856047_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

856047_en-US

856047_en-US

MMA8453 Detect false double tap

Hi,

MMA8453 is placed inside a device which a person can carry while traveling. We've enabled double tap feature which the person can use in case of emergency. The problem is we're getting false double taps when the vehicle is moving.

Configuration:

REG_PULSE_CFG 0x2A

REG_PULSE_THSX 0x20

REG_PULSE_THSY 0x20

REG_PULSE_THSZ 0x40

REG_PULSE_TMLT 0x18

REG_PULSE_LTCY 0x28

REG_PULSE_WIND 0x3C

Thanks,

Prakash

Re: MMA8453 Detect false double tap

Hi Prakash,

I have never heard of a similar problem and it is hard to provide any specific setting that would eliminate such unwanted triggers. My only recommendation is to adjust the threshold and duration values by testing it in a vehicle.

Best regards,

Tomas

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎02-04-2026 06:14 AM
更新者: