S32K344 DMAMUX1 LPUART14 BUS FAULT Hello, using S32K344 with Zephyr OS. I set a DTS for LPUART14 DTS: dmas = <&edma0 16 46>, <&edma0 17 47>; Channel 16,17 should be in DMAMUX1 range, where LPUART14 is on slot 46 and 47. Unfortunately, when ASYNC API calls callback for a next buffer (immidiatelly after uart_rx_enable) Any Idea? ERROR: [00:00:00.010,000] os: ***** BUS FAULT ***** [00:00:00.010,000] os: Precise data bus error [00:00:00.010,000] os: BFAR Address: 0x40254000 [00:00:00.010,000] os: r0/a1: 0x4020c000 r1/a2: 0x00048000 r2/a3: 0x0000001a [00:00:00.010,000] os: r3/a4: 0x0041126c r12/ip: 0x20402888 r14/lr: 0x00404393 [00:00:00.010,000] os: xpsr: 0x01000000 [00:00:00.010,000] os: s[ 0]: 0x0041126c s[ 1]: 0x00404393 s[ 2]: 0x00000010 s[ 3]: 0x00410250 [00:00:00.010,000] os: s[ 4]: 0x00000000 s[ 5]: 0x21000440 s[ 6]: 0x00000000 s[ 7]: 0x20000460 [00:00:00.010,000] os: s[ 8]: 0x00000004 s[ 9]: 0x00000010 s[10]: 0x00000020 s[11]: 0x204094c0 [00:00:00.010,000] os: s[12]: 0x204094c0 s[13]: 0x0040fa28 s[14]: 0x204094c0 s[15]: 0x404a4000 [00:00:00.010,000] os: fpscr: 0x00000000 [00:00:00.010,000] os: r4/v1: 0x20402888 r5/v2: 0x0040fa08 r6/v3: 0x00000011[0m [00:00:00.010,000] os: r7/v4: 0x20000440 r8/v5: 0x404a401c r9/v6: 0x204021d0 [00:00:00.010,000] os: r10/v7: 0x0000061c r11/v8: 0x00000020 psp: 0x20409418 [00:00:00.010,000] os: EXC_RETURN: 0xfffffffd [00:00:00.010,000] os: Faulting instruction address (r15/pc): 0x0040dc2c [00:00:00.010,000] os: >>> ZEPHYR FATAL ERROR 25: Unknown error on CPU 0 [00:00:00.010,000] os: Current thread: 0x20401e18 (main) [00:00:00.618,000] os: Halting system Re: S32K344 DMAMUX1 LPUART14 BUS FAULT Hello, Thank you very much for your help. I was also communicating with Zephyr and it seems they found a bug in eDMA driver. https://github.com/zephyrproject-rtos/zephyr/issues/96772 Re: S32K344 DMAMUX1 LPUART14 BUS FAULT Hello @PavelRydl ,
Thank you for the update and for confirming that the issue persists across multiple S32K344 modules. This helps rule out hardware-related causes. Based on the faulting instruction inside the EDMA driver (edma_reload_loop) and the crash address (0x4025803c), I have reviewed the EDMA implementation and would like to suggest the following checks and recommendations:
1. Ensure CONFIG_DMA_TCD_QUEUE_SIZE is ≥ 2 The cyclic mode requires at least two TCDs to form a valid loop. If the queue size is set to 1, the reload logic may fail.
2. Validate write_idx bounds before accessing the TCD pool The driver uses write_idx to index into the TCD pool: tcd = &DEV_CFG(dev)->tcdpool[channel][data->transfer_settings.write_idx];
Please ensure that write_idx is always less than CONFIG_DMA_TCD_QUEUE_SIZE. You may add a debug log to confirm: LOG_DBG("write_idx = %d", data->transfer_settings.write_idx);
3. Confirm buffer alignment and size Your buffer declaration: __aligned(32) uint8_t async_rx_buffer[2][RX_CHUNK_LEN]; is correct. Just ensure that RX_CHUNK_LEN is a multiple of the data unit size (e.g., 1, 2, or 4 bytes).
4. Disable cyclic mode if not required If your application does not require cyclic DMA, please ensure: config->cyclic = false This will avoid triggering the edma_reload_loop() logic entirely.
5. Enable DMA error IRQ and check error flags Make sure the DTS does not disable error IRQs (no_error_irq = false). Then monitor: EDMA_GetErrorStatusFlags(...) for any reported faults during runtime.
6. Use basic DMA mode for initial testing If cyclic or scatter-gather is not needed, consider using the basic configuration path: dma_mcux_edma_configure_basic(...) This simplifies the setup and avoids complex reload logic.
Best regards,
Pavel Re: S32K344 DMAMUX1 LPUART14 BUS FAULT I tested other module with s32k344 and same problem. It's not a hardware problem. Re: S32K344 DMAMUX1 LPUART14 BUS FAULT Hello, "If the issue persists, try replacing the DMA-based RX with polling temporarily to confirm that the UART peripheral itself is functional and the issue is isolated to DMA usage." Actually, I Used interrupt-driven uart before and it's working fine. I need DMA becuase of high CPU usage and interrupt based uart is not reliable enough, mostly becuase of really small RX FIFO buffer (4 words) "Verify uart_rx_buf_rsp() is not called too early" tested, same problem. Also, this request next buffer and I should provide it as fast as possible. "Try using async_rx_buffer[0] instead of [1]" Tested, but same problem. Reference manual says I should not bind to the same memory, so I still have to use different part of memory for a next buffer. "Try reducing the buffer size" Tested. same problem. I have no idea, what I should do now 🙂 Is it a bug in a NXP drivers? It's strange, MUX0 is fine, only MUX1. It's really like DMA cannot access somewhere, but that a bit above my current nxp knownledge to solve that. Thank you for helping me! Re: S32K344 DMAMUX1 LPUART14 BUS FAULT Hello @PavelRydl ,
Thank you sharing details.
Please find my hints below:
1. Check buffer alignment and cache settings In your code, the buffer is declared as:
__nocache __aligned(32) uint8_t async_rx_buffer[2][RX_CHUNK_LEN];
This is correct and should be DMA-safe. However, please verify that:
- RX_CHUNK_LEN is a multiple of 32 (it is 32, so OK). - The buffer is not being accessed concurrently from another context (e.g., logging or polling).
2. Verify uart_rx_buf_rsp() is not called too early Even though the callback is triggered only once, it's possible that the DMA controller hasn't finished setting up the initial transfer when uart_rx_buf_rsp() is called. Try delaying the response slightly:
case UART_RX_BUF_REQUEST: k_sleep(K_MSEC(1)); // Small delay before responding uart_rx_buf_rsp(dev, async_rx_buffer[1], RX_CHUNK_LEN); break;
3. Try using async_rx_buffer[0] instead of [1] Since [0] is the initial buffer used in uart_rx_enable(), and [1] is never used before the crash, try responding with [0] to rule out any issues with [1]:
uart_rx_buf_rsp(dev, async_rx_buffer[0], RX_CHUNK_LEN);
4. Try reducing the buffer size Although 32 bytes is small, try using 16 or 8 bytes to see if the crash behavior changes. This can help isolate whether the issue is size-related.
5. Optional Debug Step If the issue persists, try replacing the DMA-based RX with polling temporarily to confirm that the UART peripheral itself is functional and the issue is isolated to DMA usage.
Best regards,
Pavel Re: S32K344 DMAMUX1 LPUART14 BUS FAULT Faulting instruction address: .text.edma_reload_loop 0x00000000004030b8 0x1f4 zephyr/drivers/dma/libdrivers__dma.a(dma_mcux_edma.c.obj) Re: S32K344 DMAMUX1 LPUART14 BUS FAULT Hello, I did some changes. 1. I removed that variable, I don't need it. 2. The request is called only once and it crashes, so I will never assign same buffer again 3. It's not in any special section, just bss, I tried to use nocache just for a test with same error 4. I verified slots again 46 LPUART14 Transmit DMA Request 47 LPUART14 Receive DMA Request 5. Added 6. Added Error: *** Booting Zephyr OS build 69ce66d49133 *** [00:00:00.020,000] dma_mcux_edma: edma_log_dmamux: DMAMUX CHCFG 0x0 [00:00:00.020,000] dma_mcux_edma: dma_mcux_edma_get_status: DMA MP_CSR 0x3000d0 [00:00:00.020,000] dma_mcux_edma: dma_mcux_edma_get_status: DMA MP_ES 0x0 [00:00:00.020,000] dma_mcux_edma: dma_mcux_edma_get_status: DMA CHx_ES 0x0 [00:00:00.021,000] dma_mcux_edma: dma_mcux_edma_get_status: DMA CHx_CSR 0x0 [00:00:00.021,000] dma_mcux_edma: dma_mcux_edma_get_status: DMA CHx_ES 0x0 [00:00:00.021,000] dma_mcux_edma: dma_mcux_edma_get_status: DMA CHx_INT 0x0 [00:00:00.021,000] dma_mcux_edma: dma_mcux_edma_get_status: DMA TCD_CSR 0x0 [00:00:00.021,000] dma_mcux_edma: dma_mcux_edma_configure: channel is 18 [00:00:00.021,000] dma_mcux_edma: dma_mcux_edma_configure: INSTALL call back on channel 18 [00:00:00.021,000] dma_mcux_edma: dma_mcux_edma_start: START TRANSFER [00:00:00.021,000] dma_mcux_edma: edma_log_dmamux: DMAMUX CHCFG 0xaf [00:00:00.022,000] async_api: uart_callback: EVENT: 3 [00:00:00.022,000] os: ***** BUS FAULT ***** [00:00:00.022,000] os: Precise data bus error [00:00:00.022,000] os: BFAR Address: 0x4025803c [00:00:00.022,000] os: r0/a1: 0x4020c000 r1/a2: 0x0004c000 r2/a3: 0x0000403c [00:00:00.022,000] os: r3/a4: 0x40254000 r12/ip: 0x20401344 r14/lr: 0x0040316f [00:00:00.022,000] os: xpsr: 0x01000000 [00:00:00.022,000] os: s[ 0]: 0x00000000 s[ 1]: 0x00000004 s[ 2]: 0x20402800 s[ 3]: 0x20402810 [00:00:00.023,000] os: s[ 4]: 0x00000000 s[ 5]: 0x0000000f s[ 6]: 0x00000000 s[ 7]: 0x204027f0 [00:00:00.023,000] os: s[ 8]: 0x204027f0 s[ 9]: 0x0040d2b0 s[10]: 0x20402810 s[11]: 0x204027f0 [00:00:00.023,000] os: s[12]: 0x00000000 s[13]: 0x00401b87 s[14]: 0x0040d2f0 s[15]: 0x00401393 [00:00:00.023,000] os: fpscr: 0x0040e318 [00:00:00.023,000] os: r4/v1: 0x20401344 r5/v2: 0x00000012 r6/v3: 0x0040ca68 [00:00:00.023,000] os: r7/v4: 0x20000480 r8/v5: 0x404a401c r9/v6: 0x20400520 [00:00:00.029,000] os: r10/v7: 0x00000678 r11/v8: 0x00000020 psp: 0x20402750 [00:00:00.029,000] os: EXC_RETURN: 0xffffffed [00:00:00.029,000] os: Faulting instruction address (r15/pc): 0x0040317a [00:00:00.029,000] os: >>> ZEPHYR FATAL ERROR 25: Unknown error on CPU 0 [00:00:00.029,000] os: Current thread: 0x20400940 (main) [00:00:00.029,000] os: Halting system Tried to use different channel dmas = <&edma0 17 46>, <&edma0 18 47>; Re: S32K344 DMAMUX1 LPUART14 BUS FAULT Hello @PavelRydl ,
Thank you for the detailed report. Based on the provided logs and code snippet, here are a few suggestions:
1. Initialize async_rx_buffer_idx before use Ensure that async_rx_buffer_idx is explicitly initialized to 0 before calling uart_rx_enable(). Uninitialized global variables may lead to undefined behavior.
async_rx_buffer_idx = 0;
2. Correct buffer selection in UART_RX_BUF_REQUEST In the callback, you're always responding with async_rx_buffer[1], regardless of the current index. This may cause the driver to use an invalid or already active buffer. Instead, use the current index and toggle it after responding:
uart_rx_buf_rsp(dev, async_rx_buffer[async_rx_buffer_idx], RX_CHUNK_LEN); async_rx_buffer_idx ^= 1; // Toggle between 0 and 1
3. Verify DMA buffer location Ensure that async_rx_buffer is located in a memory region accessible by the DMA controller (typically in SRAM, not in .noinit or other special sections). Misplaced buffers can cause bus faults during DMA access.
4. Double-check DMA channel and DMAMUX slot mapping While channels 16 and 17 should be valid for DMAMUX1, please verify that: - These channels are not used by other peripherals. - The DMAMUX slot numbers 46 and 47 are correctly mapped to LPUART14 RX/TX in your SoC's reference manual and Zephyr's SoC integration.
5. Add a short delay before enabling RX In some cases, adding a small delay before calling uart_rx_enable() can help avoid race conditions between peripheral and DMA initialization:
k_sleep(K_MSEC(10)); uart_rx_enable(...);
6. Enable DMA and UART debug logs To get more insight into what happens before the crash, consider enabling debug logs for DMA and UART in your prj.conf:
CONFIG_DMA_LOG_LEVEL_DBG=y CONFIG_UART_LOG_LEVEL_DBG=y
Best regards,
Pavel
View full article