2181285_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2181285_en-US

2181285_en-US

NCJ29D6***JLink Error: CPU is not halted

When I used the LID2580, I was still able to use the Jlink download program normally at first, and then suddenly it didn't work, the error is as follows, please help me take a look, thank you


* JLink Info: Memory map 'after startup completion point' is active
***JLink Error: Could not start CPU core. (ErrorCode: -1)
***JLink Error: Cannot read register 15 (R15) while CPU is running
***JLink Error: Cannot read register 20 (CFBP) while CPU is running
***JLink Error: CPU is not halted
***JLink Error: Cannot read register 15 (R15) while CPU is running
Full Chip Erase Failed!

Re: NCJ29D6***JLink Error: CPU is not halted

Hello,


Hope you are doing well. Sorry for the inconvenience this might cause you but as the information of this product it's under NDA (Non-Disclosure Agreement) the information it's not public, this is not a secure channel to share any information of this device and I do not have the data as well for the same reason.

For this reason I recommend you contacting  one of our distributors available in the Distributor Network|NXP. Or if you have a direct contact who helped you with information about this product or getting the IC in a first place, please communicate directly with him/her.

I apologize for the inconveniences this might cause you.


Best Regards,

Ricardo

Re: NCJ29D6***JLink Error: CPU is not halted

Hello, I have encountered the same problem. Keil can connect to the chip, but the program cannot be downloaded successfully. Have you solved this issue? If so, I would appreciate your help.

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎03-05-2026 04:27 AM
更新者: