Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Unable to Debug dio_ToggledLED_S32K144 Example – Debug Error After Flashing Hi, I am working with S32K144 using S32 Design Studio 3.4. I tried debugging the dio_ToggledLED_S32K144 example project. The code flashes successfully, and I can see the LED toggling output initially. However, after some time, an error window appears, and after that, I am not able to continue debugging. Due to this issue, I am unable to debug the application properly. Could you please help with the following: What could be the possible reason for this debug error appearing after flashing? Is this related to debugger connection (J-Link / PEMicro), watchdog, or clock configuration? Are there any known issues with the dio_ToggledLED_S32K144 example in S32 Design Studio 3.4? What are the recommended steps to resolve this issue and debug the project correctly? Any guidance to resolve this issue would be very helpful. Thank you for your support. Re: Unable to Debug dio_ToggledLED_S32K144 Example – Debug Error After Flashing Hi Julián, Thank you for your response. Please find the details below: The issue appears after running the project for a few seconds to about one minute. Initially, the code runs correctly and the LED toggles, but after some time, a debug error window appears, and the debug session stops. When the issue occurs, I am not able to continue debugging. In some cases, I need to terminate the debug session and restart S32 Design Studio to flash the MCU again. I will recheck and confirm the PEmicro driver version. Currently, I am using the default PEmicro version installed with S32 Design Studio 3.4. To clarify, this issue is not only with the Dio example code. I created a separate user application (custom GPIO project) from scratch. In this user-created project, I enabled the following MCAL components: Mcu Port Dio Dem Ecuc In the Dio configuration, I selected RED LED (Dio channel 15). When I debug this user-created GPIO application, I face the same debug issue, similar to the one shown in the attached image. Based on this, the problem seems to be related to the debug configuration or PEmicro connection, rather than the Dio example logic itself. Please let me know if you need any additional details or logs from my side. Re: Unable to Debug dio_ToggledLED_S32K144 Example – Debug Error After Flashing Hi @KAVIN7, No, there should not be any problems with the Dio example, as the project only toggles a LED. Could you provide a bit more information about how to reproduce your issue? 1. How long are you running the project before the issue appears? 2. When the issue happens, are you able to reload the debug session and flash the MCU again? 3. Can you confirm you have the latest Pemicro version available? 4. Have you modified the project in any way? This issue seems to point to PEmicro drivers or debug configuration, as the Dio example does not configure anything related to watchdog or power modes. Best regards, Julián Re: Unable to Debug dio_ToggledLED_S32K144 Example – Debug Error After Flashing Hi @KAVIN7, Looking through your configuration, I can see you do not have any pins configured in the "UnTouchedPortPin" container. In order to be able to use the debug capabilities, the JTAG and Reset pins need to be configured in the Port driver using mechanism B. This means that the following pins/functionalities need to be added in the UnTouchedPortPin list: 4, 5, 10, 68 & 69. This may not be your root cause, since your issue appears after running the project for some time, but it does not hurt to try. Like I've said in my previous response, you can also try updating your SW. Latest versions are: S32DS: 3.6.5 S32K1 RTD: 3.0.0 Pemicro: 6.1.7  Lastly, please try sharing a log form the debug interface, as well as debug configuration, as it is very difficult to pinpoint an issue like this, as it cannot be reproduced on my side. Here is my debug configuration which seems to work correctly: Best regards, Julián Re: Unable to Debug dio_ToggledLED_S32K144 Example – Debug Error After Flashing Hi, Thank you for the information. However, I believe the issue discussed in this thread (Unable to Debug dio_ToggledLED_S32K144 Example — Debug Error…) is not the exact problem I’m facing. My issue is described in this other ticket instead, where I’m getting a PE Micro Connection Assistant error due to missing port configuration: https://community.nxp.com/t5/S32K/PE-Micro-Connection-Assistant-Error-Due-to-Missing/m-p/2303757#M56494 In my case: I created a custom GPIO application for LED toggle. I enabled only the RED LED pin in Dio/Port configuration. I did not enable the “UntouchedPortPin” debug pins (JTAG/RESET/XTAL/EXTAL). This results in the PE Micro connection failure, as shown in the attached image in that ticket. I believe the issue is related to missing port pin configuration required for debug interfaces (JTAG/RESET/XTAL/EXTAL), and not a problem with the dio example itself. I need this resolved because I cannot proceed with further implementation until the basic debug connection works. Could someone please review the linked ticket and advise on the correct pin configuration or steps to fix the debug connection issue? Thank you.
View full article
8CH-DMIC board configuration, flashing and testing on MIMXRT685-EVK Hi, I’m trying to run the dmic_multi_channel CM33 demo on EVK-MIMXRT685 with the 8-DMIC array board. Per the demo documentation, enabling the 8-DMIC board on J31 requires moving several resistors (e.g. R379, R380, R384, R389, R390, R391, R392 to 2–3). After doing this, FlexSPI Octal Flash (U19) becomes inaccessible: - LinkServer flashing fails - ROM ISP (blhost) connects, but FLEX-SPI-NOR shows Sector Size = 0 / Page Size = 0 - Flash erase/write is impossible My questions: Is this demo expected to run without Octal Flash (RAM-only workflow)? Is there an official flashing/boot procedure after the resistor changes? Are all resistor changes required, or can some remain in the default state to keep FlexSPI flash working? Right now it looks like the required DMIC hardware setup prevents normal flash programming/boot. How can I test and run the demo? Thanks for any guidance. MIMXRT685-EVK 8CH-DMIC  i.MXRT 600 Re: 8CH-DMIC board configuration, flashing and testing on MIMXRT685-EVK Hi @mlkezarev , Thank you so much for your interest in our products and for using our community. Q1:  Is this demo expected to run without Octal Flash (RAM-only workflow)? A1:   Yes. This demo is designed to run from SRAM only and does not require Octal Flash. Q2:Is there an official flashing/boot procedure after the resistor changes? A2: After the resistor changes are applied, the external Flash is physically disconnected. Therefore, flashing or booting from Flash is not supported in this hardware configuration. Q3:Are all resistor changes required, or can some remain in the default state to keep FlexSPI flash working? A3: If you want to enable 8 DMICs, all the specified resistor changes are required. I have post a pin configuration screenshot for your reference. Q4: Right now it looks like the required DMIC hardware setup prevents normal flash programming/boot. How can I test and run the demo? A4: You can run on SRAM, just like the SDK demo "evkmimxrt685_dmic_multi_channel_cm33" Best Regards MayLiu
View full article
RDB3 Linux 以太网配置 本文档为在恩智浦 S32G-VNP-RDB3 开发板上配置和测试网络连接提供了实用指南。它概述了准备硬件和软件环境、设置网络参数以及验证主板与主机系统之间通信的基本步骤。该指南还解释了板网络架构的关键方面,并提供了在 Linux 和 U-Boot 级别调整配置的说明。其目的是为从事汽车网络应用以太网支持和验证的工程师提供参考。 本文档是对之前的 S32G-VNP-RDB2 参考设计以太网支持指南的更新,其中纳入了特定于 RDB3 平台和更新 电路板支持包 版本的更改和注意事项。 S32G
View full article
在 i.MX9 板上为扩展接头启用 3.3 V 和 5 V 稳压器 该补丁系列支持 i.MX93-QSB、i.MX93-FRDM 和 i.MX91-FRDM 板上的树莓派扩展连接器使用的外部 3.3 V 和 5 V 电源轨。 这些调节器已在设备树中定义,但默认情况下处于禁用状态。通过激活它们,兼容 RPI 的扩展接头可以正确地为外部模块、HAT 和附加板供电。 董事会变更: i.MX93-QSB 启用 RPI 连接器使用的 3.3 V 和 5 V 外部供电线路。 i.MX93-FRDM 启用 RPI 连接器使用的 3.3 V 和 5 V 外部供电线路。 i.MX91-FRDM 启用 RPI 连接器使用的 3.3 V 和 5 V 外部供电线路。 目的是 为兼容 Raspberry Pi 的扩展端口提供适当的电源。 为连接外部 HAT 或模块的用户提高硬件兼容性。 对齐所有 i.MX9 参考板,为 RPI 连接器使用一致的电源树配置。
View full article
NETC IEEE 1588タイマーソフトウェアはRMの要件を満たしていません S32ZE NETCリファレンスマニュアルの「文書識別子:S32E27NETCRMリファレンスマニュアルRev. 4、2024-12-12」、3.2.5.3.1ドリフトおよびエラー調整付き通常モードでは、「通常動作中、TMR_ADD更新を除く1588タイマー構成(たとえばTMROFF_H/L)を変更するには、タイムゲートスケジューリング、時間指定出発スケジューリング、ストリームゲーティング、レートポリシングなどのTSN関連機能を無効にする必要があります。」と記載されています。しかし、gPTP ソフトウェアも NETC ドライバもこの仕様を満たしていません。 GPTP_STACK RTD Re: NETC IEEE 1588 timer software does not meet the requirement of RM NXP の gPTP ソフトウェア モジュールがありますが、正しいでしょうか? 現在の時刻を更新するために関数「EthSwt_43_NETC_CorrectPtpClk」を呼び出します。 「タイマーの修正に関する機能を提供する」ということについては話していません。 私の質問は、gPTP が EthSwt_43_NETC_CorrectPtpClk() 関数を呼び出して現在の時刻を更新している間に、802.1Qbv 機能に影響を与えないようにするにはどうすればよいかということです。 Re: NETC IEEE 1588 timer software does not meet the requirement of RM こんにちは@shuangjunzhuさん ETH ドライバー RTD2.0.1 は、次のようなタイムスタンプ用のいくつかの API 関数を含む ASR 21-11 に準拠しています。 このため、おっしゃる通りタイマーの修正に関する機能は提供されていないのではないかと思います。タイマー修正に関する機能は ASR23-11 でサポートされるようですが、ASR21-11 でそれらを使用する必要がある場合は、gPTP は要件を変更して要求を行う必要があります。 よろしくお願いいたします。 ニ Re: NETC IEEE 1588 timer software does not meet the requirement of RM ご清聴ありがとうございました。「ドライバーはこれまで、TMR レジスタから現在のタイマーを取得することだけをサポートしており、それらを構成することはサポートしていません」と述べられていますが、理解できません。OFFSET レジスタを変更する gPTP ソフトウェアはどうでしょうか?gPTP ソフトウェアでは OFFSET レジスタを必ず変更する必要があると思います。私の質問は、gPTP ソフトウェアが OFFSET レジスタを変更しようとしている間に、802.1Qbv 機能などの TSN 機能をスムーズに動作させるために、RM をどのようにフォローアップするかということです。 Re: NETC IEEE 1588 timer software does not meet the requirement of RM こんにちは@shuangjunzhuさん NETC ドライバに関するこのトピックに回答します。 - ZE の最新リリースは RM rev 3 に続く RTD 2.0.1 であり、私の知る限り、次のリリース RTD 2.0.2 も RM Rev 3 に続きます。ただし、RM バージョンに関する更新がある場合、SW チームには新旧の RM 間の変更を確認するためのチケットがあります。彼らはその変化を感知CANと思います。 - 私の知る限り、タイムスタンプはこれまでドライバーでサポートされていたもので、デフォルトのカウント TMR_CTRL[TE] = 0 と、1588 タイマー TMR_CTRL[TE] = 1 で動作する RTD 2.0.1 に追加された EthEnableFreeRunningTimer 機能です。現在のタイマーは 1588 レジスタ TMR_FRT_L/H から取得されますが、TE をどこにも設定しなかったため、ここでバグが発生しているようです (詳細については、チケット: ARTDCC1-593)。とにかく、ドライバーはこれまで、TMR レジスタから現在のタイマーを取得することだけをサポートしており、それらを構成することはサポートしていませんでした。あなたが言った主張は、ユーザーが 1588 レジスタの設定を変更したい場合にのみ発生するようです。 よろしくお願いいたします。 ニ Re: NETC IEEE 1588 timer software does not meet the requirement of RM こんにちは@shuangjunzhuさん つまり、1588 レジスタ リストを変更する前に TSN 機能を停止したいということですか? 現在のドライバでは、TSN を停止する機能をサポートしていないことがわかりました。TSN の各機能を無効にしたい場合は、各テーブルのエントリを削除する必要があるようです。例えば: - レートポリシー: Netc_EthSwt_Ip_DeleteRatePolicerTableEntry(); - Netc_EthSwt_Ip_DeleteStreamGateControlListTableEntry(); - EthSwt_43_NETC_StopTas(); よろしくお願いいたします。 ニ Re: NETC IEEE 1588 timer software does not meet the requirement of RM こんにちは@shuangjunzhuさん ETH ドライバーについてもう何もわからない場合は、このトピックから RTD を削除して、gPTP の担当者が回答できるようにしてください。 よろしくお願いいたします。 ニ Re: NETC IEEE 1588 timer software does not meet the requirement of RM こんにちは、 はい、まだ質問があります。イーサネット ドライバーの観点から 802.1Qbv を無効化/再有効化する方法の確認にご協力ください。また、このようなアクションが 802.1Qbv スケジュール サイクルの重大なトラフィック遅延を引き起こすかどうかを分析するのにご協力ください。 ありがとうございます ジェフ Re: NETC IEEE 1588 timer software does not meet the requirement of RM こんにちは、 大変助かりました。ありがとうございます。 車載のお客様にとって非常に重要な点を 1 つ強調しておきます。TSN IEEE802.1Qbv 機能を使用している場合、当然ながら、802.1Qbv の時間同期要件に従って gPTP も有効にする必要があります。 gPTP が 1 つの 802.1 Qbv スロットにある重要なトラフィックに影響を与えるかどうかが懸念されています。私たち(NXP)はそれを明確にし、その方法を提供する必要があります。これは非常に厳密かつ明確な要件です。これは状況を理解するための良い例、あるいはユースケースです。 はい、確かに、お客様が有効にしている TSN 機能がいくつあるかはわかりません。しかし、すべてのユーザーが使用できるように、解決策が必要です。お客様はユースケースに基づいて適切な選択を行うことができます。 ありがとうございます ジェフ Re: NETC IEEE 1588 timer software does not meet the requirement of RM こんにちは、 gPTP がタイマー オフセット レジスタを変更する前に TSN 機能を無効にしたいわけではありません。これは NETC RM の要件です。 お客様はNXPのRM仕様を満たすための公式ソリューションを求めています。TSN機能を無効にする方法、つまりこのような状況下でのIEEE802.1Qbv。お客様は、これはハードウェア要件とハードウェア関連のコーディングであるため、NXP によって提供されるはずだと想定しています。 ところで、あなたの提案はよく設計される必要があると思います。特に 802.1Qbv の場合、gPTP 同期アクションによってアプリケーション トラフィックが影響を受けないようにする方法。たとえば、一部のトラフィックが 1 つの Qbv スケジュール サイクル遅延する可能性はありますか? ありがとうございます ジェフ Re: NETC IEEE 1588 timer software does not meet the requirement of RM こんにちは@shuangjunzhuさん 私の観点からすると、TSN を停止する公式機能では、ETH ドライバからのこの要件を満たすことは困難です。ご覧のとおり、ポート ゲート タイム スケジュールを無効にするには、タイム ゲート有効ビットPTGSCR [TGE]をリセットするだけです。ただし、レート ポリシーなどの一部の TSN 機能では、この機能はこの表の要素に基づいて有効化/無効化されます。しかし、ETH からは、要素を削除または更新して無効にするためにこのテーブルにエントリが追加されたかどうかを知ることはできませんが、上位層ではこれをより適切に処理できます。このため、前回の回答では、各テーブルのエントリを削除する関数を呼び出すことを提案しました。 ユーザーがオプション機能(レートポリシング、ストリームゲート制御リストなど)を有効にしていない場合、関数EthSwt_43_NETC_StopTas()を使用して TSN を無効にすることができます。 とにかく、チケット ARTDCC1-607 を作成しました。何か見逃した場合に備えて、このチケットをフォローして SW チームからの分析を取得できます。RM Rev4 はまだ RTD リリースに適用されていません。このトピックに関して ETH について詳しいアイデアがない場合は、お知らせください。このCASEについては gPTP に任せ、引き続き gPTP 側からCAN回答させていただきます。 よろしくお願いいたします。 ニ Re: NETC IEEE 1588 timer software does not meet the requirement of RM こんにちは@shuangjunzhuさん 私の観点からすると、問題は有効になっている TSN 機能の数だけではありません。お客様が ASR コンテキストを使用する場合、これらの機能はマクロによってプリコンパイル時に有効/無効にされるだけでなく、各機能にも存在するためです。ご存知のとおり、レート ポリシング、ストリーム ゲートなどの各機能は、以下の表を通じて制御されます。 ユーザーが構成ツールで要素を構成しただけの場合、SW チームは、この機能を無効にするときに、エントリ ID を持つエントリをいくつ削除するかを制御できます。しかし、ユーザーが関数を呼び出して要素を追加した場合、SW はそれを知る方法がありません。しかし、ユーザーはアプリケーションからこれを制御できると思います。何か見逃したのかもしれませんが、TSN はタイマー値を参照するので、タイマー構成を変更する前に停止し、新しいタイマー値を取得するために再度開始するのが理にかなっていると理解しています。SW チームはそのチケットを分析する際に深い洞察力を発揮できると信じています。 よろしくお願いいたします。 ニ Re: NETC IEEE 1588 timer software does not meet the requirement of RM こんにちは、 あなたはまだ私の質問を理解していないようですね。より詳しい説明をお願いします。お客様が Qbv 構成を持っており、それが以下のパラメータで実行状態にあると仮定します。 1. サイクルタイムは10msです 2. 10 ミリ秒の期間内に、それぞれ 5 ミリ秒のスロットが 2 つあります。つまり、ゲート リストには 2 つのエントリがあります。 3. 最初のタイムスロットが開いている間に、NETC が重要なフレームを送信していると仮定します。この時点で gPTP は現在の時刻の更新を開始します。RM 要件に従って、お客様は 802.1Qbv を無効化/再度有効化する必要があります。 4. 802.1Qbv が再度有効になった後、NETC ハードウェアが引き続きタイム スロット 1 を開いたり、ゲート リストの 2 番目のエントリに移動したり、新しい Qbc スケジュール サイクルを待機したりする可能性があります。ハードウェアが 2 番目のエントリに進むと、NETC キュー内の重要なフレームが次の 10 ミリ秒サイクルで送信されることを意味します。そして、大きな遅延が発生し、アプリケーションに影響を及ぼす可能性があります。 5. お客様はこのような状況を回避する方法を尋ねています。つまり、アプリケーションへの影響を軽減するために、Qbv をスムーズに無効化/再有効化する方法です。 物事が明らかになることを望みます。 ありがとうございます Re: NETC IEEE 1588 timer software does not meet the requirement of RM こんにちは@shuangjunzhuさん 802.1 Qbv の機能は NETC とスイッチの両方をサポートしていることがわかりました。したがって、この機能は次の方法で設定できます。 - Eth_NETC: - ポートスイッチ: 機能は次のとおりです。 ETH_NETCの場合: - Eth_43_NETC_StartTas() - Eth_43_NETC_StopTas() ポートスイッチの場合: - EthSwt_43_NETC_StartTas() - EthSwt_43_NETC_StopTas() この質問「この種のアクションが 802.1Qbv スケジュール サイクルの 1 つで重大なトラフィック遅延を引き起こすかどうかを分析する」については、私の観点からすると、この機能を有効/無効にする関数 Netc/PortSwt_Ip_ConfigPortTimeGateScheduling() を見るとわかるように、この機能を無効にするには、1 ビットをリセットするだけで、この機能を有効にするには、ゲート タイムを有効にして、ゲート タイム テーブルを設定する必要があります。今回は計測可能です。 「 802.1Qbv スケジュール サイクルの 1 つ」とは、ゲート制御リストの実行時間を繰り返す必要があるという意味だと理解していますか?そうであれば、これを設定することができます。 よろしくお願いいたします。 ニ Re: NETC IEEE 1588 timer software does not meet the requirement of RM こんにちは、 前回の返信で述べた 2 つの機能以外に、TAS を有効/無効にする別の方法は見つかりませんでした。私の観点からすると、タイム ゲート制御を無効にすると、時間間隔、サイクルなどのすべての機能も無効になります。TAS の無効化と有効化の間の期間には、gPTP からのタイマーの更新を完了するまでの時間が含まれます。TAS を有効にすると、ベース時刻が現在の時刻に更新されます。ただし、新しいベース時間 = 次の古い間隔時間でない場合は、要件を確認できません。 これについてはもうわかりませんが、SW チームがあなたのCASEについて提案できるように、上記のチケットでこの質問も更新しました。 よろしくお願いいたします。 ニ
View full article
eIQ 时间序列工作室入门指南 本实验将指导您如何使用 eIQ 时间序列工作室(TSS),这是一款集成于 eIQ 工具包 的全新工具,用于为嵌入式微控制器开发时间序列模型。实验内容涵盖:时间序列数据导入方法、工具如何生成多种机器学习算法,以及如何将生成的模型部署至开发板。本实验基于 FRDM-MCXN947 开发板,但相同步骤适用于所有 eIQ 时间序列工作室 支持的设备。 MCX FRDM-MCXA153 FRDM-MCXN947 MCX-N9XX-EVK i.MX RT i.MXRT685-EVK i.MXRT595-EVK MIMXRT1060-EVK MIMXRT1170-EVK MIMXRT1180-EVK LPC LPC55S69-EVK Kinetis FRDM-K66F FRDM-KV31F FRDM-K32L3A6 DSC MC56F83000-EVK MC56F80000-EVK   您还可以观看下方的视频,以快速了解 Time Series Studio 的流程。 (在 “我的视频” 中查看) 您还可通过 App Code Hub 获取 ML 通用数据记录器 工具,用于收集可与时间序列工作室配合使用的传感器数据。 i.MX RT
View full article
无法将 iMX93EVK 中的 lpuart1 更改为 lpuart7 在过去的一个多月里,我一直在尝试将默认控制台从 lpuart1 更改为 lpuart7。我想更改 linux 控制台和 u-boot 控制台,或者至少我想查看日志。这是为了让 iMX93EVk 的 SOC 在新的载体上工作。然而,我却无法做到这一点。这是我尝试使用的补丁。还有我发现的所有我认为可以帮助我的帖子。我错过了什么? i-MX-93-91-使用yocto项目调试控制台重定位 i-MX-Processors/Change-UART-for-imx93-in-uboot-and-kernel i-MX 处理器/imx8ULP 将 u-boot 串行控制台从 UART5 更改为 UART4 非常感谢你们的帮助,谢谢 Linux Re: Cant change lpuart1 to lpuart7 in iMX93EVK 你好 要成功地将调试控制台从 lpuart1 更改为 lpuart7,你需要修改三个关键元器件:U-启动、Arm 可信固件和 Linux 内核配置。 完整解决方案: 1.对于 U-Boot(lf_v2024.04 分支): - 修改设备树文件以更新控制台路径和引脚配置 - 更新板配置以指向 lpuart7 - 使用 imx93_11x11_evk_defconfig 作为配置基础 2. 对于 Arm 可信固件(lf_v2.10 分支): - 更改 ATF 源中的 UART 控制台位置 - 更新 IMX_LPUART_BASE 以指向 lpuart7 的基址 - 在取消设置 LDFLAGS 后使用 "make plat=imx93" 构建 3. 对于 Linux 内核: -将 bootargs 更新为引用 ttylP6(对应于 lpuart7) -更新设备树中的选定部分 该过程需要使用这些修改后的元器件重建 flash.bin 映像。另一位客户需要将 i.MX93 上的 UART1 重新映射到 UART8,也成功解决了类似问题。 此致 Re: Cant change lpuart1 to lpuart7 in iMX93EVK 谢谢,我无法确认该解决方案是否有效。我已经执行了您的所有更改,但发现错误出在硬件本身。一旦定制载体修好了,一切都测试好了,我就可以确认了。 感谢您的回复
View full article
lwip 实践 您好, 我正在使用 s32K148 开发板并使用以太网功能。 请将这两个项目也发给我,它们似乎对我也有帮助, lwip_s32k148_HandsOn_Server lwip_s32k148_HandsOn_Client 这两个例程在网上都找不到。 我的邮箱是 [email protected] 期待您的回复。 Re: lwip HandsOn 你好@G_Z、 我给你发了一条私信。 lwip HandsOn 请将这两个项目发给我。 lwip_s32k148_HandsOn_Server lwip_s32k148_HandsOn_Client 我的电子邮件是 [email protected] Re: lwip HandsOn 谢谢您! Re: lwip HandsOn 你好,@lengrudie、 我已就这些项目给您发送了私人信息。 致以最崇高的敬意, Julián。
View full article
S32K3 SAF - sCheck_ExecuteStartupTests 运行到 HardFault Execption 您好,技术支持、 客户分享了 一个问题,即在启动时调用 sCheck_ExecuteStartupTests(),之后在执行 ECC 测试时会跳转到硬故障异常。 您能帮忙检查一下这一点吗? MCU: S32K314 SAFETY_SW Re: S32K3 SAF - sCheck_ExecuteStartupTests run to HardFault Execption 你好@marcuslim, 对于每个 sCheck 测试,都必须遵循 sCheck UM 章节中描述的所有条件: L1 CACHE ECC 测试 在这种情况下,很可能是内存部分的位置和适当的 MPU 设置有误,这对正确执行该测试非常重要。 更多详情,请参阅 sCheck UM 章节: 内存分配(将内存分配到具有正确的可缓存或不可缓存 MPU 属性的部分至关重要) ,您还可以在 SAF 演示示例中探索链接器文件和 MPU 设置。 亲切的问候, Radoslav Re: S32K3 SAF - sCheck_ExecuteStartupTests run to HardFault Execption 嗨,拉多斯拉夫、 Cusotmer 将恩智浦示例中的 sCheck_ExecuteRuntimeTests() 替换为 sCheck_ExecuteStartupTests(),结果遇到了类似的错误。 能否请您明确说明我可以在哪里检查? Re: S32K3 SAF - sCheck_ExecuteStartupTests run to HardFault Execption 嗨 @marcuslim 不,你不能通过在专用的用于运行时测试的循环中替换 sCheck 启动测试来使用。 启动测试只应在应用程序启动过程开始时执行一次。 此外,SAF 演示示例不支持 K314,因此,如果您重复使用了某些链接器文件,它很可能不会遵循 K314 设备的内存映射,需要进行更新。 SAF 不容易内置,需要认真学习 sCheck 手册并了解软件功能安全概念。 亲切的问候, Radoslav Re: S32K3 SAF - sCheck_ExecuteStartupTests run to HardFault Execption 嗨,拉多斯拉夫、 客户反馈: 不过,我们目前遇到了与 ECC 检查有关的问题。您可能已经注意到,恩智浦示例中也出现了类似的 ECC 检查问题。 内置SAF软件包非常具有挑战性,因此,我们将感谢恩智浦专家在这方面的支持。 您能否就我们需要遵循和验证的与链接器相关的具体要点或要求提出建议,以便正确内置 ECC 检查? 提前感谢您的帮助。 Re: S32K3 SAF - sCheck_ExecuteStartupTests run to HardFault Execption 你好,Marcus, ,所有信息都应该从 sCheck UM 中清楚地了解到,至少我通常不会遇到这类问题,所以 SAF 团队认为 sCheck UM 在这方面是清楚的。 您能否询问客户 sCheck UM 到底有哪些不清楚的地方,以便我们改进? 谢谢, Radoslav Re: S32K3 SAF - sCheck_ExecuteStartupTests run to HardFault Execption 嗨,拉多斯拉夫、 客户将 *(.ramcode_no_cacheable) 从 int_sram_no_cacheable 移至 int_sram,结果运行正常。 如有任何意见,请随时提出。 根据 表 55.sCheck 模块中的 MemMap 部分, 以下部分必须放在特定的闪存区域中: s32_saf_const_flash_0 → 代码闪存 0 s32_saf_const_flash_1 → 代码闪存 1 s32_saf_const_flash_2 → 代码闪存 2 s32_saf_const_flash_3 → 代码闪存 3 不过,在我的系统中,我使用的是 A/B 交换因此,在任何时候都只有 闪存 0 和 闪存 1 被应用程序激活/使用。 放置 s32_saf_const_flash_2 和 s32_saf_const_flash_3 和 32_saf_const_flash_3 可能会干扰未使用的闪存区域(例如,为其他闪存组或 OTA 更新预留的闪存区域)。 我的问题是 是否有办法配置 sCheck,使其只在 Flash 0 和 Flash 1 上执行测试? 或者 是否有安全的方法来测试所有四个闪存块(闪存 0-3),而不影响 A/B 交换使用的非活动库的内容? 的内容? Re: S32K3 SAF - sCheck_ExecuteStartupTests run to HardFault Execption 嗨,拉多斯拉夫、 除了上一篇文章中提出的问题外,客户还分享说,在执行sCheck_ExecuteStartupTests和sCheck_ExecuteRuntimeTests 之后,系统始终报告同一组与 ECC 相关的错误: scheck_err_dcache_ecc_cm7_0 scheck_err_icache_ecc_cm7_0 SCHECK_ERR_ITCM_M7_0_ECC SCHECK_ERR_DTCM_M7_0_ECC 在每次测试执行过程中,这些错误都会反复出现。 能否请您协助我们调查并确定这种行为的根本原因? 敬上, 马库斯 Re: S32K3 SAF - sCheck_ExecuteStartupTests run to HardFault Execption 嗨 @marcuslim, 将 *(.ramcode_no_cacheable)从 int_sram_no_cacheable 移至 int_sram 起作用可能有点巧合。 我怀疑如果客户将 HFNMIENA 设置为 0,则在触发信号时可能会造成麻烦。 请检查一下 MPU_CTRL.HFNMIENA 的值是多少。 如果该值为零,则已针对即将发布的 1.0.6 版本进行了以下修复: [ASFT-19327] [sCheck] 不支持 Arm M7 HFNMIA - 恩智浦 JIRA sCheck 闪存测试不能仅缩减为 Flash_0 和 Flash_1,但已对即将发布的 1.0.6 版本进行了更改,无需将特定的闪存部分放入链接器文件中,而是使用配置的闪存地址,其中地址的内容不会被修改,这也可以解决 A/B 交换客户的问题。 https://jira.sw.nxp.com/browse/ASFT-19738 此致, 拉多斯拉夫 Re: S32K3 SAF - sCheck_ExecuteStartupTests run to HardFault Execption 你好@marcuslim ,我认为有一个共同的根源。 内存部分需要根据可缓存/不可缓存 MPU 属性正确放置,上一篇文章中提到的 HFNMIENA 位也会造成问题。 亲切的问候, Radoslav Re: S32K3 SAF - sCheck_ExecuteStartupTests run to HardFault Execption 嗨,拉多斯拉夫、 客户尝试重新定位 *(.ramcode_no_cacheable)。 到 int_sram_noo_cacheable 而不是 内存 并将 HFNMIENA = 0。 此外,还对 MPU 进行了适当配置,以允许从不可缓存 RAM 区域执行代码。 经过进一步调查,发现在 sCheck_Tcm_RunEccTest 中的函数 sCheck_Tcm_MemTestEccCorrError 和 sCheck_Tcm_MemTestUncorrError 函数将被执行。 这两个函数都调用 sCheck_ErrRead(pParams,&result)。 但是,当 sCheck_Tcm_MemTestEccCorrError 成功完成、 scheck_tcm_memtestuncorrerRror 在 调用 scheck_errRead(PParams,& 结果)(附图中的第 1 点)时会 触发 HardFaul t, 系统随后卡在 BusFault 处理程序 (所附图像中的第 2 点) 中。 能否请您帮助调查一下这一点? Re: S32K3 SAF - sCheck_ExecuteStartupTests run to HardFault Execption 嗨 @marcuslim, 对不起我错了,你的 SAF 版本中的正确设置应为 HFNMIENA = 1,以避免在异常中更改 MPU 设置,这可能会进一步导致缓存之后刷新一些变化。这就解释了为什么 TCM correctable 可以通过,而 Uncorrectable 不能通过,因为它使用异常来测试正确的反应。 亲切的问候, Radoslav Re: S32K3 SAF - sCheck_ExecuteStartupTests run to HardFault Execption 嗨,拉多斯拉夫、 客户反馈: >>>>>>>> 配置HFNMIENA = 1 后,我发现sCheck_ExecuteStartupTests()可以正常运行。此时,我不再观察到任何与 ECC 相关的错误。我将进行额外的压力测试,以进一步验证这种行为。 但是,当调用 sCheck_ExecuteRuntimeTests() 并随后调用 sCheck_Tcm_MemTestUncorrError() 时,系统会在设置 INVSTATE(无效状态)标志的情况下触发信号 UsageFault 异常。 请问sCheck_ExecuteStartupTests()和sCheck_ExecuteRuntimeTests()之间是否存在任何设计上的差异或特定的使用条件,会导致这种行为? 此致, 马库斯 Re: S32K3 SAF - sCheck_ExecuteStartupTests run to HardFault Execption 您好@marcuslim, 如果启用了 FPU,这可能表明存在参数问题,我们需要进一步调查。 您能否尝试禁用 FPU 并重新进行测试? 现在结果如何? 启用 FPU 后,能否在 Watch 窗口的异常跟踪中使用这些变量: sCheck_ErrRead_ExceptionContext.bAbortFlag sCheck_DetectedFaults[0] 并再次粘贴截图? FCCU NCF_2 通道的配置反应是什么? , Radoslav。 Re: S32K3 SAF - sCheck_ExecuteStartupTests run to HardFault Execption 嗨,拉多斯拉夫、 请在此提供所需的信息: 要点 1:禁用 FPU - 同样的错误。 要点 2:启用 FPU 第 3 点:FCCU NCF_2 反应 此致, 马库斯 Re: S32K3 SAF - sCheck_ExecuteStartupTests run to HardFault Execption 你好,马库斯、 最新截图显示,它产生的是内存管理故障,而不是使用故障(如原帖所示)。因此,我认为我们需要澄清我们面临的例外情况是什么。 请检查/共享 MPU 配置。 你能检查一下异常是否由"LDRD R0,R1,[R1]\n" 指令(来自 sCheck_Lib_ARMv7M.c 或其他指令)引起的吗? 亲切的问候, Radoslav Re: S32K3 SAF - sCheck_ExecuteStartupTests run to HardFault Execption 嗨,拉多斯拉夫、 附上客户的 MPU 配置和链接器文件。他希望我们对其进行审查。 此致, 马库斯 Re: S32K3 SAF - sCheck_ExecuteStartupTests run to HardFault Execption 嗨 @marcuslim, 我看到他们重复使用了 RTD 示例 systemInit () 中的 MPU 配置。 请注意,这只是 RTD 的短截线,未经验证,即使对于某些 RTD 驱动程序来说也可能不够,更不用说 SAF 了。 同样,对于链接器文件,我可以看到来自RTD链接器文件的来源,以及额外的SAF和SCST内存部分。 关于 MPU 配置,我强烈建议使用 RTD Platform 插件配置 MPU。 在 SAF 演示示例中,我们还提供了 K344 的 MPU 配置示例(不是 K314,但只需修改 TCM 的正确内存大小)。 但它也只是 SAF Demo 设置的示例代码(短截线),未经过验证的交付内容。 按照人工智能的要求,他们的 MPU 配置应该代表这种设置: 地区 RBAR 地址 大小 类型/缓存政策 可共享 门禁系统 说明 0 0x00000000 覆盖整个地址空间(RASR = 0x1004003F ) 强烈订购,无缓存 是 无访问 背景区域阻挡一切 1 __INT_ITCM_START 来自链接器 正常,无缓存 无 RW/RW 用于 CM7 的 ITCM 2 __ROM_CODE_START 来自链接器 正常,WB/WA(内侧& 外侧) 无 RO/RO 主程序闪光 3 __ROM_DATA_START 来自链接器 正常,WB/WA 是 RO/RO 数据闪存 4 0x1B000000 8 KB ( 0x160B0019 ) 正常,WB/WA 是 RO/RO UTEST 地区 5 __INT_DTCM_START 来自链接器 正常,无缓存 无 RW/RW CM7 的 DTCM 6 __INT_SRAM_START 来自链接器的大小 ( __RAM_CACHEABLE_SIZE ) 正常,WB/WA 无 RW/RW 可高速缓存 SRAM(禁用子区域 6 和 7) 7 __RAM_NO_CACHEABLE_START 来自链接器 正常,无缓存 是 RW/RW 非缓存 RAM 区域 8 __RAM_SHAREABLE_START 来自链接器 正常,无缓存 是 RW/RW 可共享内存 9 0x40000000 6MB 强烈订购,无缓存 是 RW/RW AIPS0-2 外围空间(禁用第 6/7 分区) 10 0x40600000 S32K314 已禁用 — — — AIPS3;仅在 S32K39x 上有效 11 0x67000000 128 MB 强烈建议 是 RW/RW QSPI RX 12 0x68000000 128 MB 正常,WB/WA 无 RW/RW QSPI AHB 映射区域 13 0xE0000000 默认 ARM PPB 大小 强烈建议 是 RW/RW 私人外围总线(SCB、NVIC 等) 14 __ROM_CODE_START + 0x400000 S32K314 为 0 — — — 附加程序闪光灯(仅对其他衍生产品有效) 15 0x44000000 S32K314 为 0 — — — ACE 区域仅在 S32K388 上活跃 这是 K344 的 SAF 演示示例中的 MPU 配置: 简单比较这两个 MPU 配置 + 链接器文件可以看出: -这些内存部分的位置不正确:* (.s32_saf_const_flash_1) * (.s32_saf_const_flash_2) * (.s32_saf_const_flash_3) * (.s32_saf_const_flash_4) * (.s32_saf_const_const_flash_4) * (.s32_saf_const_const_flash_4) * (.s32_saf_const_const_flash_4) * (.s32_flash_5)-看不到不可缓存的 SRAM 的可执行属性,但这不是 sCheck 所要求的,这可能是 SAF 示例 MPU 设置中的冗余属性——考虑到客户正在运行操作系统,我预计操作系统及其需要一些特定的 MPU 设置和内存部分 应用程序(只是猜测,并不是说这可能是某些问题的根本原因) 无论如何,客户应遵循 SAF 用户手册和 RTD 手册第 " 章内存分配 " 进行正确的 MPU 和链接器文件设置,重复使用恩智浦示例中的短截线不是一个好做法。 特别是当操作系统在 sCheck 测试期间运行时,还需要按照 sCheck 章节" Exclusive Areas(在 BSW Scheduler" 中定义的专属区)进行测试。eMcem 和 RTD 驱动程序中也有类似的排他性区域。 亲切的问候, Radoslav
View full article
HSEコンセプト こんにちは、NXPさん M7 と A53 から HSE に並行してアクセスするために、内部で同期が行われますでしょうか?完全に分離されていますか? M7 で SHE 仕様に従って HSE が使用され、A53 で pkcs11 に従って HSE が使用される場合、理論的にはそれらは互いのキーにアクセスできますか (一部の暗号化に同じキーを使用)?SHE でキーをプロビジョニングして、それを他のパーティションで使用することはできますか? s32g274を使用したカスタムボード よろしくお願いいたします。 あんぱ Re: HSE concept こんにちは、 @anpa711 ご投稿ありがとうございます。 1. 通常、M7 部分は 1 つの MU を介して HSE にアクセスしますが、A53 部分は別の MU を介して並行して HSE にアクセスする場合があり、HSE は内部ロジックに基づいてこれらの要件を処理し、ユーザーには透過的です。 2. HSE では、SHE キーは HSE_KEY_TYPE_SHE であり、共通操作は HSE_KEY_TYPE_AES である可能性がありますが、これらは HSE では異なるタイプであり、SHE 操作は SHE サービス経由でのみプロビジョニングできるため、 HSE_KEY_TYPE_SHE タイプのキーをエクスポートすることはできません。 BR チェイン Re: HSE concept こんにちは、 @anpa711 ご返信ありがとうございます。 はい、可能です。 BR チェイン Re: HSE concept こんにちは、 @anpa711 ご返信ありがとうございます。 1. S32G の観点からは、HSE_DEMOAPP に含まれる SHE ベースのセキュア ブート デモのみが提供されています。これは、NXP アカウントの HSE FW ダウンロード ページから入手できます。 2. S32K の部分については、あまり詳しくないので申し訳ありませんが、返信は、この掲示板に返信した同僚によって提供されるはずです: https://community.nxp.com/t5/S32K/bd-p/S32K BR チェイン Re: HSE concept こんにちは、 chenyin_hさん ありがとう、これは良さそうです。 s32K および s32g の MCAL には、SHE 仕様 (EB Autosar スタックと MCAL を使用しています) に従って、または他の形式で、いくつかのキー プロビジョニング デモ/テストが付属していますか? よろしくお願いいたします。 あんぱ Re: HSE concept こんにちは、 chenyin_h さん 回答ありがとうございます。 1. わかりました。同期は必要ないようですね。 2. キーを抽出するつもりはなく、次のUSE CASEを意味しました。SHE 仕様では、AES キーをスロット 8 にプロビジョニングします。このキーが存在する場合、A53 側でこのキーを使用して pkcs11 を使用して復号化/暗号化します。これは可能ですか? よろしくお願いいたします。 あんぱ
View full article
操作指南:在 S32G 电路板支持包中配置静态 IP 1. 简介 当使用由电路板支持包(如 BSP43)生成的 Yocto 根文件系统时,默认的网络配置通常设置为使用 DHCP。因此,S32G-VNP-RDB3 板上连接到每个端口的 DHCP 服务器可能会为不同的以太网端口分配不同的 IP 地址。 这种默认行为对大多数客户来说很方便,因为它不需要额外的网络配置。端口在连接以太网电缆后立即可用,这与已包含DHCP服务器的典型开发环境非常吻合。 然而,有些客户可能没有可用的 DHCP 服务器,或者他们需要特定的网络配置,而不是使用 DHCP 自动分配的设置。例如,客户可能希望将某个以太网端口专门用于某个子网,以便通过 SSH 进行访问。在无法使用 UART 调试控制台的情况下,预先设置好静态 IP,便可在开发板启动后立即进行远程访问。 本文档介绍了一种方法,可为某个特定以太网端口配置静态 IP 地址,同时让其余端口继续使用默认的 DHCP 配置。客户还可以进一步定制配置以满足其具体的网络需求。 S32G
View full article
RT1021:使用 ROM_FLEXSPI_NorFlash_Erase() 擦除闪存扇区 你好 在 EVK 上,我试用了 SDK 25.03.00 中的 evkmimxrt1020_fsl_romapi 示例,它工作正常。 然后,我自己在另一个项目中进行了尝试。它失败了。 ROM_FLEXSPI_NorFlash_Erase() 返回 6001,表示 kStatus_ROM_FLEXSPI_InvalidSequence。 我不知道是哪个顺序。 这两个项目使用完全相同的结构: config->memConfig.tag = FLEXSPI_CFG_BLK_TAG; config->memConfig.version = FLEXSPI_CFG_BLK_VERSION; config->memConfig.readSampleClksrc=kFLEXSPIReadSampleClk_LoopbackInternally; config->memConfig.serialClkFreq = kFLEXSPISerialClk_30MHz; /* Serial Flash Frequencey.See System Boot Chapter for more details */ config->memConfig.sflashA1Size = FLASH_SIZE; config->memConfig.csHoldTime = 3U; /* Data hold time, default value: 3 */ config->memConfig.csSetupTime = 3U; /* Date setup time, default value: 3 */ config->memConfig.deviceType = kFLEXSPIDeviceType_SerialNOR; /* Flash device type default type: Serial NOR */ config->memConfig.deviceModeType = kDeviceConfigCmdType_Generic; config->memConfig.columnAddressWidth = 0U; config->memConfig.deviceModeCfgEnable = 0U; config->memConfig.waitTimeCfgCommands = 0U; config->memConfig.configCmdEnable = 0U; /* Always enable Safe configuration Frequency */ config->memConfig.controllerMiscOption = FSL_ROM_FLEXSPI_BITMASK(kFLEXSPIMiscOffset_SafeConfigFreqEnable); config->memConfig.sflashPadType = kSerialFlash_4Pads; /* Pad Type: 1 - Single, 2 - Dual, 4 - Quad, 8 - Octal */ config->pageSize = FLASH_PAGE_SIZE; config->sectorSize = FLASH_SECTOR_SIZE; config->blockSize = FLASH_BLOCK_SIZE; config->ipcmdSerialClkFreq = kFLEXSPISerialClk_30MHz; /* Clock frequency for IP command */ /* Fast Read Quad I/O */ config->memConfig.lookupTable[4U * NOR_CMD_LUT_SEQ_IDX_READ + 0U] = FSL_ROM_FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xebU, RADDR_SDR, FLEXSPI_4PAD, 0x18U); config->memConfig.lookupTable[4U * NOR_CMD_LUT_SEQ_IDX_READ + 1U] = FSL_ROM_FLEXSPI_LUT_SEQ(DUMMY_SDR, FLEXSPI_4PAD, 0x06U, READ_SDR, FLEXSPI_4PAD, 0x4U); /* Read Status */ config->memConfig.lookupTable[4U * NOR_CMD_LUT_SEQ_IDX_READSTATUS] = FSL_ROM_FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x05U, READ_SDR, FLEXSPI_1PAD, 0x1U); /* Write Enable */ config->memConfig.lookupTable[4U * NOR_CMD_LUT_SEQ_IDX_WRITEENABLE] = FSL_ROM_FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x06U, STOP, FLEXSPI_1PAD, 0x0U); /* Page Program - quad mode */ config->memConfig.lookupTable[4U * NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM + 0U] = FSL_ROM_FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x32U, RADDR_SDR, FLEXSPI_1PAD, 0x18U); config->memConfig.lookupTable[4U * NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM + 1U] = FSL_ROM_FLEXSPI_LUT_SEQ(WRITE_SDR, FLEXSPI_4PAD, 0x04U, STOP, FLEXSPI_1PAD, 0x0U); /* Sector Erase */ config->memConfig.lookupTable[4U * NOR_CMD_LUT_SEQ_IDX_ERASESECTOR] = FSL_ROM_FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xD7U, RADDR_SDR, FLEXSPI_1PAD, 0x18U); /* Block Erase */ config->memConfig.lookupTable[4U * NOR_CMD_LUT_SEQ_IDX_ERASEBLOCK] = FSL_ROM_FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xD8U, RADDR_SDR, FLEXSPI_1PAD, 0x18U); 此外,在这两个项目中,我在调用 ROM_FLEXSPI_NorFlash_Erase() 之前立即验证了 LUT。这些值完全匹配(我还打印了未打包的值): 0: a1804eb - 1 0 eb - 2 2 18 1: 26043206 - c 2 6 - 9 2 4 2: 0 - 0 0 0 - 0 0 0 3: 0 - 0 0 0 - 0 0 0 4: 406 - 1 0 6 - 0 0 0 5: 0 - 0 0 0 - 0 0 0 6: 0 - 0 0 0 - 0 0 0 7: 0 - 0 0 0 - 0 0 0 8: d33e7f5c - 1f 3 5c - 34 3 3e 9: 450ef151 - 3c 1 51 - 11 1 e 10: 46d155d4 - 15 1 d4 - 11 2 d1 11: 73a1e822 - 3a 0 22 - 1c 3 a1 12: 47bf75f6 - 1d 1 f6 - 11 3 bf 13: a1f5786b - 1e 0 6b - 28 1 f5 14: ed50a7ab - 29 3 ab - 3b 1 50 15: fdf85725 - 15 3 25 - 3f 1 f8 16: 3de09612 - 25 2 12 - f 1 e0 17: 73b47a1d - 1e 2 1d - 1c 3 b4 18: 5cd51237 - 4 2 37 - 17 0 d5 19: 86c0494b - 12 1 4b - 21 2 c0 20: 36343fa5 - f 3 a5 - d 2 34 21: 60d6ddf4 - 37 1 f4 - 18 0 d6 22: fa5745bf - 11 1 bf - 3e 2 57 23: 45fbf74d - 3d 3 4d - 11 1 fb 24: 755471dc - 1c 1 dc - 1d 1 54 25: d5a578c4 - 1e 0 c4 - 35 1 a5 26: 11330943 - 2 1 43 - 4 1 33 27: de5431f6 - c 1 f6 - 37 2 54 28: 2404049f - 1 0 9f - 9 0 4 29: 0 - 0 0 0 - 0 0 0 30: 0 - 0 0 0 - 0 0 0 31: 0 - 0 0 0 - 0 0 0 32: 81750f57 - 3 3 57 - 20 1 75 33: c25ccbf0 - 32 3 f0 - 30 2 5c 34: 8235cd11 - 33 1 11 - 20 2 35 35: 107dccd7 - 33 0 d7 - 4 0 7d 36: c3dde31f - 38 3 1f - 30 3 dd 37: 52185d05 - 17 1 5 - 14 2 18 38: c558911f - 24 1 1f - 31 1 58 39: 6d076d06 - 1b 1 6 - 1b 1 7 40: ad5b6f74 - 1b 3 74 - 2b 1 5b 41: c5d5fe5e - 3f 2 5e - 31 1 d5 42: 80654f09 - 13 3 9 - 20 0 65 43: 407951c6 - 14 1 c6 - 10 0 79 44: b456e9a3 - 3a 1 a3 - 2d 0 56 45: 41a8df34 - 37 3 34 - 10 1 a8 46: f31f6b95 - 1a 3 95 - 3c 3 1f 47: 87dddb44 - 36 3 44 - 21 3 dd 48: 3d917153 - 1c 1 53 - f 1 91 49: 1d205437 - 15 0 37 - 7 1 20 50: 48256685 - 19 2 85 - 12 0 25 51: 546d7544 - 1d 1 44 - 15 0 6d 52: 75741a5c - 6 2 5c - 1d 1 74 53: 7115f5fd - 3d 1 fd - 1c 1 15 54: 4cdff553 - 3d 1 53 - 13 0 df 55: 27c647eb - 11 3 eb - 9 3 c6 56: 7e4c0413 - 1 0 13 - 1f 2 4c 57: 303f0784 - 1 3 84 - c 0 3f 58: 25f045b8 - 11 1 b8 - 9 1 f0 59: a5898157 - 20 1 57 - 29 1 89 60: 4715e747 - 39 3 47 - 11 3 15 61: 554858c4 - 16 0 c4 - 15 1 48 62: cd44c644 - 31 2 44 - 33 1 44 63: 50597dd9 - 1f 1 d9 - 14 0 59 我深信一定存在差异,但我已不知道该去哪里寻找。 两个项目都在 RAM 中运行,时钟配置完全相同。 我应该把问题的重点放在哪里? 此致问候 最大值 i.MX RT102x Re: RT1021: Erasing flash sector using ROM_FLEXSPI_NorFlash_Erase() 您好@Sam_Gao 我解决了它。问题出在错误的擦除地址上,但错误代码kStatus_ROM_FLEXSPI_InvalidSequence却让我想到了一个完全不同类型的问题,因此我在相当长的一段时间里都把注意力放在了错误的事情上。 顺祝商祺! 最大值 Re: RT1021: Erasing flash sector using ROM_FLEXSPI_NorFlash_Erase() @mastupristi https://mcuxpresso.nxp.com/api_doc/dev/4490/a00017.html#ga05dc3f1fb8704a958f48f18ad04c2f0f 这似乎是无效序列中的一些问题。我能知道这两个项目是否都来自恩智浦的官方示例,并在同一个EVK板上为你进行了测试吗?
View full article
imx95 verdin-evk mlan/moal サポート こんにちは、リストの皆さん 次のボードの Wi-Fi/Bluetooth をサポートするために、Linux-imx カーネルと mwifiex コンポーネントのタグlf-6.6.3-1.0.0 を使用しています。 8<-- U-Boot SPL 2023.04+gf8a2983ec8+p0 (2024年3月4日 - 07:25:04 +0000) SOC: 0xa1009500 LC: 0x40010 SYS ブート理由: por、発生元: -1、エラー: -1 SYS シャットダウン理由: por、発生元: -1、エラー: -1 DDRMIXがパワーアップしました 通常のブート MMC1から起動しようとしています プライマリセットが選択されました MMC/SD 0xacc00からイメージをロードする お知らせ: BL31: v2.8(リリース):android-14.0.0-imx95-demo-1-g8dbe28631 通知: BL31: 構築日時: 2024年1月22日 17:57:56 U-Boot 2023.04+gf8a2983ec8+p0 (2024年3月4日 - 07:25:04 +0000) CPU: i.MX95 rev1.1(1800MHz) CPU: オートモーティブ温度グレード (-40℃~125℃)、22℃ LM ブート理由: por、origin: -1、errid: -1 LM シャットダウン理由: por、発生元: -1、エラー: -1 モデル: Toradex i.MX95 19X19 TITAN EVK [..] -->8 私はimx95-19x19-titan.dtbを使用していますが、この dtb にノードがなくても Wi-Fi がどのようにサポートされるのか疑問に思っています。この dtb を逆コンパイルすると、Bluetooth 用のノードが 1 つあります (動作していません)。 8<-- [..] シリアル番号@42590000 { 互換性 = "fsl,imx95-lpuart", "fsl,imx8ulp-lpuart", "fsl,imx7ulp-lpuart"; <0x42590000 0x1000> レジスタ<0x00 0x42 0x04> =; 割り込み<0x11 0x90> =; クロック =; クロック名 = "ipg"; dmas<0x27 0x16 0x00 0x01 0x27 0x15 0x00 0x00> =; dma-names = "rx", "tx"; ステータス = "正常"; pinctrl-names = "デフォルト"; ピンコントロール-0 =<0x2e> �; ファンドル =<0xcf> �; ブルートゥース { 互換性 = "nxp、88w8987-bt"; fw-init-baudrate<0x2dc6c0> =; }; }; [..] -->8 しかし、Wi-Fi のノードがありません。 どうすれば正常に動作するのでしょうか? モジュール mlan と moal をロードすると「正常」になりますが、新しいネットワーク インターフェースがありません。 8<-- root@target-imx95-verdin-evk:~# modprobe moal mod_para=nxp/wifi_mod_para.conf drvdbg=0x7 [ 1451.671079] mlan: ツリー外のモジュールをロードするとカーネルが汚染されます。 [ 1451.705854] wlan: MWLANドライバを読み込んでいます [ 1451.709988] wlan: バス ドライバに登録... [ 1451.714385] wlan: バスドライバへの登録が完了しました [ 1451.718855] wlan: ドライバが正常にロードされました -->8 何か手がかりはありますか? ありがとうございます。よろしくお願いします。 Re: imx95 verdin-evk mlan/moal support こんにちは@ebio 、 ご反応いただきありがとうございます。 toradex (git://git.toradex.com/linux-toradex.git)からカーネルリポジトリを取得します。ブランチtoradex_6.6-2.2.x-imxを選択し、カーネルをビルドします。 imx カーネル リポジトリとは対照的に、「wifi」を含む dtb ファイル名がいくつかあります。 8<-- % arch/arm64/boot/dts/freescale -iname "imx95*wifi*.dtb" を検索 arch/arm64/boot/dts/freescale/imx95-verdin-nonwifi-mallow.dtb arch/arm64/boot/dts/freescale/imx95-verdin-nonwifi-dev.dtb arch/arm64/boot/dts/freescale/imx95-verdin-wifi-ivy.dtb arch/arm64/boot/dts/freescale/imx95-verdin-nonwifi-ivy.dtb arch/arm64/boot/dts/freescale/imx95-verdin-wifi-dev.dtb arch/arm64/boot/dts/freescale/imx95-verdin-wifi-mallow.dtb arch/arm64/boot/dts/freescale/imx95-verdin-nonwifi-dahlia.dtb arch/arm64/boot/dts/freescale/imx95-verdin-nonwifi-yavia.dtb arch/arm64/boot/dts/freescale/imx95-verdin-wifi-dahlia.dtb arch/arm64/boot/dts/freescale/imx95-verdin-wifi-yavia.dtb -->8 ご想像のとおり、Toradexから必要なものを抽出し、NXPカーネルリポジトリ(タグ: lf-6.6.3-1.0.0)のDTBを適応させようとしています。😞 8<-- diff --git a/arch/arm64/boot/dts/freescale/imx95-19x19-evk.dts b/arch/arm64/boot/dts/freescale/imx95-19x19-evk.dts インデックス ccb88efde3c1..859183be58dc 100644 --- a/arch/arm64/boot/dts/freescale/imx95-19x19-evk.dts +++ b/arch/arm64/boot/dts/freescale/imx95-19x19-evk.dts @@ -189,6 +189,20 @@ reg_usdhc2_vmmc: レギュレータ-usdhc2 { アクティブハイを有効にする; }; + /* Wi-Fi を追加 */ + reg_wifi_en: レギュレーター Wifi-en { + 互換 = 「レギュレータ固定」; + pinctrl-names = "default"; + pinctrl-0 = <&pinctrl_wifi_pwr_en>; + /* PMIC_EN_WIFI */ + gpios = <&gpio1 11 GPIO_ACTIVE_HIGH>; + アクティブハイを有効にする; + レギュレータ最大マイクロボルト = <3300000>; + レギュレータ最小マイクロボルト = <3300000>; + レギュレータ名 = "PDn_MAYA-W260"; + 起動遅延時間 = <2000>; + }; + reg_pcie0: レギュレータ-pcie { compatible = "レギュレータ固定"; レギュレータ名 = "PCIE_WLAN_EN"; @@ -676,6 +690,19 @@ &usdhc2 { ステータス = "正常"; }; +/* Wi-Fiサポートを追加 */ +/* モジュール内 Wi-Fi */ +&usdhc3 { + pinctrl-names = "default", "state_100mhz", "state_200mhz"; + ピンctrl-0 = <&pinctrl_usdhc3>; + ピンctrl-1 = <&pinctrl_usdhc3>; + pinctrl-2 = <&pinctrl_usdhc3_200mhz>; + 電源を停止したままにします。 + 取り外し不可。 + vmmc-supply = <&reg_wifi_en>; + ステータス = "正常"; +}; + &enetc_port0 { pinctrl-names = "デフォルト"; pinctrl-0 = <&pinctrl_enetc0>; @@ -1142,6 +1169,32 @@ IMX95_PAD_SD2_DATA3__USDHC2_DATA3 0x13fe IMX95_PAD_SD2_VSELECT__USDHC2_VSELECT 0x51e >; }; + + + /* WB SKU ではモジュール内 Wi-Fi、それ以外の場合はモジュール固有の SDIO */ + pinctrl_usdhc3: usdhc3grp { + fsl,ピン = , /* SD3_CLK */ + , /* SD3_CMD */ + , /* SD3_DATA0 */ + , /* SD3_DATA1 */ + , /* SD3_DATA2 */ + ; /* SD3_DATA3 */ + }; + + pinctrl_usdhc3_200mhz: usdhc3-200mhzgrp { + fsl,ピン = , /* SD3_CLK */ + , /* SD3_CMD */ + , /* SD3_DATA1 */ + , /* SD3_DATA2 */ + , /* SD3_DATA3 */ + ; /* SD3_DATA4 */ + }; + + pinctrl_wifi_pwr_en: wifipwrengrp { + /* PMIC_EN_WIFI */ + fsl、ピン = ; + }; + }; &vpuctrl { -->8 ご想像のとおり、動作しません。 nxp カーネル タグ 6.6.3-1.0.0 では、なぜ nxp は dtb を提供しないのでしょうか? ドキュメントhttps://www.nxp.com/docs/en/user-guide/UG10163.pdfに驚きました第11.1章/11.3章wifi/bluetooth カーネル モジュールをロードする方法を説明します。このドキュメントはカーネルタグLF6.12.34_2.1.0に基づいていることを知っていますしかし、同じハードウェア サポートが提供されると期待できます。 また、カーネルと imx95-verdin-wifi-dev.dtb の起動を試みましたが、scmi の非互換性のため失敗しました。 この問題を解決するのに NXP についてが適切な会社なのか、それとも Toradex の方が優れているのか教えてください。 ありがとうございます。よろしくお願いします。 Re: imx95 verdin-evk mlan/moal support こんにちは、 Linux カーネル タグ lf-6.6.3-1.0.0 を使用する i.MX95 プラットフォームの場合、88w8987 モジュールの WiFi サポートには適切なデバイス ツリー構成が必要です。デバイス ツリーには Bluetooth ノードがありますが、WiFi ノードがないためインターフェースが表示されません。 WiFi では、88w8987 モジュールと適切にインターフェースするために、デバイス ツリー内に SDIO ノードが必要です。mlan および moal モジュールをロードすると、ログに「ドライバが正常にロードされました」と表示されるため正常にロードされますが、適切なデバイス ツリー構成がないとハードウェアを検出できないため、ネットワーク インターフェースを作成できません。 1. デバイスツリーファイル(imx95-19x19-titan.dtb)にSDIOノードを追加する必要があります。88w8987 モジュールの WiFi コンポーネントを参照します。 2. ノードには通常、次のものが含まれます。 - SDIOコントローラの互換文字列 - 移動できないプロパティ - システムのサスペンド中も電源をオンにしたままにする - WiFi固有の設定 3. WiFi ノードと Bluetooth ノードの両方を含む i.MX8MM EVK など、88w8987 をサポートする他の i.MX ボードの既存の実装を参照します。 Toradex ボードを使用している場合は、i.MX95 モジュールで WiFi を有効にするために推奨されている特定の実装の詳細については、Toradex のドキュメントも確認することをお勧めします。 よろしくお願いします。 Re: imx95 verdin-evk mlan/moal support こんにちは、リストの皆さん 自分自身に答えています^^。 linux-imx 用のタグlf-6.6.3-1.0.0で WiFi を作成するには、次の手順に従います。 コミット483162118e93に従って、ファイルarch/arm64/boot/dts/freescale/imx95-19x19-titan.dtsを変更します。 8<-- diff --git a/arch/arm64/boot/dts/freescale/imx95-19x19-titan.dts b/arch/arm64/boot/dts/freescale/imx95-19x19-titan.dts インデックス 38f985d5f87c..3c0a2708114e 100644 --- a/arch/arm64/boot/dts/freescale/imx95-19x19-titan.dts +++ b/arch/arm64/boot/dts/freescale/imx95-19x19-titan.dts @@ -18,6 +18,18 @@ ダミーレジスタ: ダミーレジスタ { レギュレータ最小マイクロボルト = <3300000>; レギュレータ最大マイクロボルト = <3300000>; }; + + usdhc3_pwrseq: usdhc3_pwrseq { + 互換性 = "mmc-pwrseq-simple"; + リセットgpio = <&i2c7_pcal6524_23 11 GPIO_ACTIVE_HIGH>; + }; + + /delete-node/ reg_serdes_stby; + /delete-node/ レギュレータ MAC スタンバイ; + /delete-node/ reg_m2_pwr; + /delete-node/ reg_slot_pwr; + /delete-node/ レギュレータ-m2-pwr; + /delete-node/ レギュレータスロット電源; }; &reg_can1_stby { @@ -48,11 +60,40 @@ &reg_aqr_en { gpio = <&i2c7_pcal6524_23 21 GPIO_ACTIVE_HIGH>; }; +&reg_pcie0 { + /delete-property/ vin-supply; + gpio = <&i2c7_pcal6524_23 18 GPIO_ACTIVE_HIGH>; +}; + +&pcie0 { + リセットgpio = <&i2c7_pcal6524_23 17 GPIO_ACTIVE_LOW>; +}; + +&pcie1 { + /delete-property/ vpcie-supply; + リセットgpio = <&i2c7_pcal6524_23 16 GPIO_ACTIVE_LOW>; +}; + +&pcie1_ep { + /delete-property/ vpcie-supply; +}; + &reg_serdes_en { vin-supply = <&dummy_reg>; gpio = <&gpio4 28 GPIO_ACTIVE_LOW>; }; +&usdhc3 { + pinctrl-names = "default"; + ピンctrl-0 = <&pinctrl_usdhc3>; + mmc-pwrseq = <&usdhc3_pwrseq>; + vmmc-電源 = <&reg_pcie0>; + バス幅 = <4>; + 電源を停止したままにします。 + 取り外し不可。 + ステータス = "正常"; +}; + &enetc_port1 { pinctrl-names = "デフォルト"; pinctrl-0 = <&pinctrl_enetc1>; @@ -161,4 +202,15 @@ pinctrl_pwm_3_dsi_hpd_gpio: dsihpdgrp { IMX95_PAD_GPIO_IO12__GPIO2_IO_BIT12 0x31e >; }; + + pinctrl_usdhc3: usdhc3grp { + fsl、ピン = < + IMX95_PAD_SD3_CLK__USDHC3_CLK 0x158e + IMX95_PAD_SD3_CMD__USDHC3_CMD 0x138e + IMX95_PAD_SD3_DATA0__USDHC3_DATA0 0x138e + IMX95_PAD_SD3_DATA1__USDHC3_DATA1 0x138e + IMX95_PAD_SD3_DATA2__USDHC3_DATA2 0x138e + IMX95_PAD_SD3_DATA3__USDHC3_DATA3 0x138e + >; + }; -->8 リポジトリhttps://github.com/nxp-imx/mwifiex/からドライバをコンパイルします。タグ lf-6.6.3-1.0.0で、 mlan.ko moal.koをターゲットディレクトリ /usr/lib/modules/6.6.3-gccf0a99701a7/updates/ にコピーします。 https://github.com/nxp-imx/imx-firmware.gitからタグ lf-6.6.3-1.0.0のファームウェアを取得し、 sduart_nw61x_v1.bin.se をターゲットディレクトリ /lib/firmware/nxp/ にコピーします。 ターゲットにモジュールをロードするには 8<-- root@imx95-19x19-lpddr5-evk:~# modprobe moal mod_para=nxp/wifi_mod_para.conf drvdbg=0x7 [..] [ 2690.237289] NXP 802.11 アダプタ uap0 を登録 [ 2690.250018] NXP 802.11 アダプタ wfd0 を登録 [ 2690.254421] wlan: バージョン = SDIW612---18.99.2.p66.17-MM6X18437.p3-GPL-(FP92)-dbg [ 2690.267643] wlan: バスドライバへの登録が完了しました [ 2690.272323] wlan: ドライバが正常にロードされました [..] --->8 新しいネットワーク インターフェースmlan0、uap0、wfd0が作成されます。 チケットを閉じることができます。 これが役に立つことを願います。 よろしくお願いします。
View full article
访问 nxp.com 您好。 如果不使用VPN,就无法访问nxp.com功能域的所有站点。 我收到了错误信息: Access Denied You don't have permission to access "http://mcuxpresso.nxp.com/en/dashboard" on this server. Reference #18.977a7b5c.1754475329.7d13ec17 https://errors.edgesuite.net/18.977a7b5c.1754475329.7d13ec17 也许这些都是按 IP 地址设置停止列表的错误。 恩智浦公司有谁能解决这个问题? Re: Access to nxp.com   同样的问题 您没有权限访问该服务器上的"http://www.nxp.com/" 。 参考 #18.633c655f.1754500173.c79a737 https://errors.edgesuite.net/18.633c655f.1754500173.c79a737
View full article
MBDT:S32K144 - 无此文件或目录 你好 我刚刚在计算机上安装了 MATLAB 2025b,并安装了与恩智浦 S32K1XX 配合使用的所有附加组件,我尝试使用"gpio-S32K144" 示例,结果出现了文件错误(目录错误或不存在错误)。 请帮帮我 谢谢! Re: MBDT: S32K144 - No such file or directory 您好 @mariuslucianand : 感谢您的回答。 您知道哪些恩智浦附加组件与 2025b 兼容并经过测试吗? 1.尝试删除 gpio_s32k144_mbd_rtw 文件夹和 slprj 文件夹,然后再次尝试生成代码。 -> 没有变化,仍有错误 2.尝试卸载工具箱,然后将其安装到一个没有空格的更短路径中,然后再试一次。为此,您可以首先调整设置 -> MATLAB -> Add-Ons 中 Intallation 文件夹下的 MATLAB Add-Ons 设置。 -> 我修改了C:\Users\stefp\AppData\Roaming\MathWorks\MATLAB_Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx中的添加路径。 还是同样的错误,但现在使用的工具链是"MinGW64 | gmake (64 位 Windows)" ,我已经没有 S32DS GCC 选项了。 Re: MBDT: S32K144 - No such file or directory 你好,@StephP、 首先,我想提一下,适用于 S32K1 的 MBDT 已于 2022 年发布,它仅在 R2016a 到 R2022a 的 MATLAB & Simulink 版本上进行了测试,这些版本在发布之日上市。不幸的是,目前没有计划发布针对R2025b的版本。但是,我尝试在R2025b上运行相同的示例,它生成了.el f文件。 现在,我看了一下你的日志,有一些建议你可以试试。 1.尝试删除 gpio_s32k144_mbd_rtw 文件夹和 slprj 文件夹,然后再次尝试生成代码。 2.尝试卸载工具箱,然后将其安装到一个没有空格的更短路径中,然后再试一次。为此,您可以首先调整设置 -> MATLAB -> Add-Ons 中 Intallation 文件夹下的 MATLAB Add-Ons 设置。 希望这能帮到您, Marius
View full article
S32K1xx:Frequent access to eeprom sends hardfault Hello,     In the development process encountered a problem, frequent access to the S32K118 analog eeprom sent hardfault, I know frequent write eep without delay will occur errors, frequent read will also? The snippet code is as follows:     for (uint8 i = 0; i < 16u; i++)     {         u8slog[i] = *((uint8 *)(0x14000000) + i) ;     } Re: S32K1xx:Frequent access to eeprom sends hardfault Hi @ZEROOO, Reading the FlexRAM does not require any delay, even in the EEE mode, it is just an SRAM. But instead of valid data, the read access can return all 0xFF if there is an ECC error in the backup flash. So, the application should check if the data are valid before they are processed further. Writing does not require any delay per se, it requires the CCIF flag to be set before the FlexRAM in the EEE mode can be written. Regards, Daniel Re: S32K1xx:Frequent access to eeprom sends hardfault Hello, Yes, frequent reads from the S32K118's analog EEPROM, even without writes, can potentially lead to issues and even hard faults. Here's a breakdown of why and how to mitigate it: Understanding the S32K118 Analog EEPROM Not a Standard Memory: The analog EEPROM on the S32K118 is not like standard RAM or flash. It's an emulated EEPROM using flash memory, and it has specific characteristics that must be considered. Limited Endurance: Even read operations can contribute to the wear and tear of the underlying flash memory cells. While reads don't cause the same level of stress as writes, repeated reads over time can still degrade the flash. Access Timing: The analog EEPROM access, especially reads, might require specific timing considerations. If reads are performed too rapidly without allowing sufficient time for the memory to stabilize, it can lead to errors. Bus Conflicts: Very frequent reads can potentially cause bus conflicts or timing issues, especially if other peripherals or processes are also accessing the memory bus. This can manifest as a hard fault. Why Frequent Reads Can Cause Issues Flash Wear (Though Minor): While writes are the primary cause of flash wear, repeated reads can also contribute, albeit to a much lesser extent. The flash memory cells are still subjected to electrical stress during read operations. Timing and Bus Contention: The memory controller needs time to access and retrieve data from the flash memory. If reads are performed too rapidly, it might not be able to keep up, leading to data corruption or bus errors. If other peripherals are also accessing the memory bus, frequent reads can exacerbate bus contention, potentially leading to hard faults. Potential for Software Errors: If the read operation is not handled correctly in the software, it can lead to errors. For example, reading beyond the valid address range or not checking for errors can cause issues. Analyzing Your Code Snippet for (uint8 i = 0; i < 16u; i++) { u8slog[i] = *((uint8 *)(0x14000000) + i); } This code reads 16 bytes sequentially from the analog EEPROM address range starting at 0x14000000. If this code is executed very frequently without any delays, it could contribute to the problems mentioned above. Mitigation Strategies Introduce Delays: Add small delays between read operations to allow the memory controller to stabilize. The necessary delay will depend on the specific characteristics of the S32K118's analog EEPROM. Example:   #include "S32K118.h" // Include header file for delay functions. for (uint8 i = 0; i < 16u; i++) { u8slog[i] = *((uint8 *)(0x14000000) + i); //Add a small delay. for(volatile uint32_t delay = 0; delay < 1000; delay++){} //example delay. } Note that the delay amount will need to be tuned for your specific application. Using a timer based delay is preferable to a simple loop delay. Read Less Frequently: If possible, reduce the frequency of read operations. Cache the data in RAM if it doesn't change frequently. Check for Errors: Implement error checking to detect any read errors. The S32K118 might have status registers or flags that indicate memory access errors. Optimize Bus Usage: Minimize bus contention by optimizing the timing of other peripheral accesses. If possible, use DMA to reduce the CPU load during memory access. Refer to the Datasheet: Consult the S32K118 datasheet and reference manual for specific timing requirements and recommendations for analog EEPROM access. Verify Address Range: Ensure that the address range that you are reading from is valid. Reading from an invalid address range will cause a hardfault.
View full article
S32 Design Studio v3.5 安装回滚问题 我正在尝试在公司设备(Windows 11)上安装 S32 Design Studio v3.5,一旦安装量达到 6%,它就会回滚并且安装失败。我遵循了以下社区帖子中提供的一些建议 S32 设计回滚安装错误 - NXP 社区 如"以管理员身份运行" 并启用完全控制"C:\Users\name\AppData\Local\Temp" 我附上日志供您参考,请帮助解决这个问题。 激活 | 安装 | 许可 | 安装程序下载 Re: S32 Design Studio v3.5 installation rollback issue "以管理员身份运行" 这个 exe 文件,似乎就能解决问题。如果没有帮助,我建议您咨询 IT 部门。
View full article
clrc663 lpcd i 和 q 值 i 得到 0x00 我正在使用 clrc663 作为读卡器我在那里实现了 lpcd 模式我在运行 lpcd 校准功能时遇到了问题我得到了 i 而且 q 值是 0x00 我从天线得到的是什么问题怎么解决这个问题 我使用的这个函数   /* 执行 LPCD 校准 */ phStatus_t Calibrate_LPCD(uint32_t dwLPCDDemo, uint32_t *pdwLPCDRefValue) { phStatus_t wStatus; uint8_t bValueI = 0; uint8_t bValueQ = 0; uint8_t bVersion = 0; uint8_t bDigitalFilter = PH_ON; uint16_t wDetectionOption = PHHAL_HW_RC663_FILTER_OPTION1; uint16_t wPowerDownTimeMs = LPCD_POWERDOWN_TIME; uint16_t wDetectionTimeUs = LPCD_FIELD_ON_DURATION; DEBUG_PRINTF("\nLPCD 校准开始。"); phhalHw_FieldOn(pHal); phhalHw_Wait(pHal, PHHAL_HW_TIME_MILLISECONDS, 5);   /* 配置 LPCD 模式默认值,以执行 LPCD 校准循环。 * 提供输入参考 I 和 Q 值为零,并将检测时间提供给 * 在此持续时间内打开射频,使用 I 和 Q 通道值测量负载变化。 * 配置合适的掉电时间以节省 RC663 读卡器IC 的功耗。*/ wStatus = phhalHw_Rc663_Cmd_Lpcd_SetConfig(pHal,PHHAL_HW_RC663_CMD_LPCD_MODE_DEFAULT、 bValueI、bValueQ、wPowerDownTimeMs、wDetectionTimeUs); CHECK_STATUS(wStatus); DEBUG_PRINTF("\nphhalHw_Rc663_Cmd_Lpcd_SetConfig."); /* 读取版本寄存器,以区分 RC663 Old(RC66301、RC66302)和 RC663 Plus(RC66303)。*/ wStatus = phhalHw_Rc663_ReadRegister(pHal,PHHAL_HW_RC663_REG_VERSION,&bVersion); DEBUG_PRINTF("\nphhalHw_Rc663_ReadRegister."); CHECK_STATUS(wStatus); 如果 (bVersion == PHHAL_HW_CLRC663PLUS_VERSION)     { /* 配置充电泵,使其具有较高的检测范围。 * 启用电荷泵会在检测阶段增加功率级 * 探测范围。这导致平均电流消耗增加。*/ wStatus = phhalHw_SetConfig(pHal,PHHAL_HW_RC663_CONFIG_LPCD_CHARGEPUMP,PH_ON); CHECK_STATUS(wStatus); DEBUG_PRINTF("\nphhalHw_SetConfig."); /* 配置数字滤波器会触发信号 RC663 Plus 算法以获得倍数的平均值 * 检测 I 值和 Q 值的变化。这反过来又延长了射频开启时间 * 增加平均电流消耗。*/ wStatus = phhalHw_SetConfig(pHal,PHHAL_HW_RC663_CONFIG_LPCD_FILTER、 ((uint16_t)(bDigitalFilter)|wDetectionOption)); CHECK_STATUS(wStatus);    }   /* 执行 LPCD 校准周期并获取 LPCD 参考 I 和 Q 值。*/ wStatus = phhalHw_Rc663_Cmd_Lpcd_GetConfig(pHal,&bValueI,&bValueQ); DEBUG_PRINTF("\nphhalHw_Rc663_Cmd_Lpcd_GetConfig."); CHECK_STATUS(wStatus);   *pdwLPCDRefValue = ((bValueI) | (bValueQ<< 0x8)); DEBUG_PRINTF("\npdwLPCDRefValue.");   DEBUG_PRINTF("\nLPCD 校准成功。");   返回 PH_ERR_SUCCESS; } 然后我在主 while 循环中调用 /* ------------------------------------------------------------------ * 开机后运行一次 LPCD 校准 * ------------------------------------------------------------------ */ phStatus_t LPCD_Calibrate(void) { phStatus_t status; uint32_t refVal; char dbg_buf[64]; // 确保在校准前开启 RF phhalHw_FieldOn(pHal); phhalHw_Wait(pHal,PHHAL_HW_TIME_MILLISECONDS,5); status = Calibrate_LPCD(LPCD_DEMO_MODE_DEFAULT,&refVal); // 校准后关闭射频 phhalHw_FieldOff(pHal); if (status == PH_ERR_SUCCESS) { gLpcdValueI = (uint8_t)(refVal& 0xFF); gLpcdValueQ = (uint8_t)((refVal 0xFF)); gLpcdValueQ = (uint8_t)((refVal 0xFF)).>> 😎 & 0xFF); gLpcdCalibrated = 1; sprintf(dbg_buf,"LPCD Calibration OK (I=0x%02X, Q=0x%02X)\r\n", gLpcdValueI, gLpcdValueQ); DEBUG_UART2((unsigned char*)dbg_buf, strlen(dbg_buf)); } else { DEBUG_UART2((unsigned char*)"LPCD Calibration FAILED\r\n", 28); } return status; } 如果 (!lpcdCalibrated)     { 如果 (LPCD_Calibrate() == PH_ERR_SUCCESS) { lpcdCalibrated = 1; // 标记为已完成 DEBUG_UART2((unsigned char*)"LPCD Calibration OK\r\n", 23);          } 不然 { DEBUG_UART2((unsigned char*)"LPCD Calibration FAILED\r\n", 28);      }    } Re: clrc663 lpcd i and q value i getting 0x00   您好,先生, 非常感谢您与我们分享您的示意图。不过,我还是要问一下你们天线的史密斯图。我们确实有一份应用笔记,其中显示了使用廉价的纳米VNA进行这些测量的步骤。 Re: clrc663 lpcd i and q value i getting 0x00 我在这里附上我的硬件测试和原理图,在正常模式下,我得到的是 uid,这不是问题;在 lpcd 模式下,我得到的是 0x00,0x00 的 q 值。在此查看我的测试文件。 Re: clrc663 lpcd i and q value i getting 0x00 抱歉,但是对自定义板的支持非常有限。   要提供任何具体信息,我需要您的硬件,因为评估套件的天线设置配置与您的配置存在很大差异。   不过,您是否介意分享一下天线的史密斯图和原理图,这将是我们提供良好建议的一个很好的起点。   正如我在上一篇文章中提到的那样,我们建议从一开始就遵循一些步骤。其中之一是将我们的 EVK 与您的新天线和新的匹配电路一起使用。所有这些都显示在我们的许多文档中。请看 NFC天线设计|恩智浦半导体视频2。   发送 RF 开启命令后,I 和 Q 值应显示与 0x0 不同的值。 Re: clrc663 lpcd i and q value i getting 0x00 我使用的是带有 stm32 硬件的定制 PCB Clrc663,只有在软件中天线调谐是正确的,我使用了 nfcrdlibEx6_rc663_LPCD_Demo.c 库中的校准演示代码,但 i 和 q 值均为 0x00,然后我使用错误寄存器来确定我在其中出现了什么错误。 printf debug i getting === EEPROM / LPCD 检查开始 === VERSION(0x7F)=0x1A ERROR(before)=0x00 ERROR(after LOADREG)=0x80 > > > EEPROM 错误 (0x80) 仍然存在。LPCD 可能无法正确校准! === EEPROM / LPCD 检查完成 === // 这是代码 phStatus_t Rc663_EepromInitAndCalibrateLPCD( phhalHw_Rc663_DataParams_t *pHal, uint32_t *pdwLPCDRefValue) { phStatus_t status; uint8_t bVersion, bIrq1, bErr; uint8_t bValueI = 0, bValueQ = 0; char dbg[64]; uint8_t eepromVal; uint8_t addr; sprintf(dbg,"\r\n=== EEPROM + LPCD Init ===\r\n"); DEBUG_UART2((uint8_t*)dbg, strlen(dbg)); /* 1.读取芯片版本 */ status = phhalHw_Rc663_ReadRegister(pHal, PHHAL_HW_RC663_REG_VERSION,&bVersion); CHECK_STATUS(status); sprintf(dbg,"VERSION(0x7F)=0x%02X\r\n", bVersion); DEBUG_UART2((uint8_t*)dbg, strlen(dbg)); /* 2.清除任何现有错误 */ phhalHw_Rc663_ReadRegister(pHal, PHHAL_HW_RC663_REG_ERROR,&bErr); sprintf(dbg,"ERROR(before)=0x%02X\r\n", bErr); DEBUG_UART2((uint8_t*)dbg, strlen(dbg)); /* 3. 强制将 LOADREG 从 EEPROM 写入寄存器 */ status = phhalHw_Rc663_WriteRegister(pHal, PHHAL_HW_RC663_REG_COMMAND, PHHAL_HW_RC663_CMD_LOADREG); CHECK_STATUS(status); /* EEPROM 加载稍有延迟 */ phhalHw_Wait(pHal, PHHAL_HW_TIME_MILLISECONDS, 5); /* 4.再次检查错误寄存器 */ phhalHw_Rc663_ReadRegister(pHal, PHHAL_HW_RC663_REG_ERROR,&bErr); sprintf(dbg,"ERROR(after LOADREG)=0x%02X\r\n", bErr); DEBUG_UART2((uint8_t*)dbg, strlen(dbg)); if (bErr& PHHAL_HW_RC663_BIT_EE_ERR) { sprintf(dbg,"> > > EEPROM 错误 (0x%02X) detected!\r\n" 、berR); DEBUG_UART2 ((uint8_t*) dbg、strlen (dbg)); /*---EEPROM 转储(前 16 个字节用于调试)---*/ for (addr = 0;addr < 0x10;addr++) { phalHW_rc663_cmd_reade2 (phAL,addr,1,& eePromade2) val); spr intf (dbg," EEPROM [0x%02X] = 0x%02X\ r\n ",addr,eepromVal);DEBUG_UART2 ((uint8_t*) dbg,strlen (dbg));} /*---绕过 EEPROM 继续手动初始化---*/ sprintf (dbg," 绕过 EEPROM,使用手动 RF 设置...\ r\n "); DEBUG_UART2 ((uint8_t*) dbg、strlen (dbg));phhalHW_rc663_WriteRegister(phal,PHHAL_HW_RC663_RC663_REGISTER,PHAL_HW_RC663_RC663_RC663_); phalHW_RC663_WriteRegister REG_TXAMP,0x1F);phhalHW_RC663_WriteRegister(phal,PHHAL_HW_RC663_REG_DRVCON,0x18);} else {sprintf(dbg," EEPROM LOADREG OK。 \ r\n "); DEBUG_UART2 ((uint8_t*) dbg,strlen (dbg));} /* 5. 清除 IRQ 标志 */ phHALHW_RC663_WriteRegister(phal、PHHAL_HW_RC663_REG_IRQ0、0x7F);phalHW_RC663_WriteRegister(phal、PHHAL_HW_RC663_REG_IRQ1、0x7F);/* 6。 启用校准模式 */ phHALHW_RC663_WriteRegister (phAL、PHHAL_HW_RC663_REG_LPCD_OPTIONS、0x02);/* 7. 启动 LPCD_CALIBRATE(0x37 是隐藏的校准命令)*/ phhalHW_RC663_WriteRegister( phal,PHHAL_HW_RC663_REG_COMMAND,0x37);/* 8。 等待 LPCDIRQ */ 做 {phHalHW_rc663_readRegister ( phAL、PHHAL_HW_RC663_REG_IRQ1、& birQ1);} while (! (birQ1 & PHHAL_HW_RC663_BIT_LPCDIRQ)); /* 9. 读取 I/Q 结果 */ phHALHW_RC663_readRegister(phal、PHHAL_HW_RC663_REG_LPCD_RESULT_I、& bValueI);phalHW_rc663_readRegister(phal、PHHAL_HW_RC663_REG_LPCD_RESULT_Q、& bValueQ);/* 10。 存储 */ *pdwLPCDRefValue = (uint32_t)bValueI | ((uint32_t)bValueQ<< 8); sprintf(dbg,"[LPCD] 校准完成:I=0x%02X Q=0x%02X Ref=0x%08X\r\n", bValueI, bValueQ, *pdwLPCDRefValue); DEBUG_UART2((uint8_t*)dbg, strlen(dbg)); return PH_ERR_SUCCESS; } Re: clrc663 lpcd i and q value i getting 0x00 您好,先生, 为了校准 CLRC663 的 LPCD,我们强烈建议您使用NFC Cockpit。 这是一个图形用户界面工具,允许用户以图形方式对天线进行微调,同时进行LPCD 校准(第 4.5 节)。我们鼓励您使用这种方法,因为校准必须根据您自己的设计进行。没有任何手册可以按部就班地完成这一程序。 NFC Cockpit 允许用户在读写器卸载和加载时进行实时校准。 请探讨查看以下天线设计视频系列的第 4 段视频的可能性:NFC 天线设计 | 恩智浦半导体
View full article
ADV7535:显示屏上无图像输出 嗨,团队、 我们正在基于 Verdin Yavia IMX8M Plus 的定制载板上开发 DSI 转 HDMI 变流器 ( ADV7535)。 我们已经替换了 ADV7535 而不是 LT8912B MIPI DSI 转 HDMI 桥接器 ,后者自带 Toradex 载板。我们使用 I2C 通道 2 与 ADV7535 DSI 转 HDMI 桥接器进行 通信,这与使用不同的 I2C 通道的 Yavia 载板不同。因此,我们对设备树进行了以下更新以反映这一变化: 设备树变更 1. verdin-imx8mp_dsi-to-hdmi_overlay.dts 删除现有 hdmi_lontium_lt8912 节点。 在 I2C2 节点下新增 hdmi_adv7535 节点。 2. imx8mp-verdin.dtsi 删除了 hdmi_lontium_lt8912 节点。 从 hdmi_connector 节点中删除了 Lontium 引脚连接细节。 已添加 hdmi_adv7535 作为 I2C2 下的子节点。   更改后的观察结果 成功读写 ADV7535 的内部寄存器。 能够转储 I2C 数据: torizon@verdin-imx8mp-15404184:~$ i2cdump -y -f 1 0x39 No size specified (using byte-data access) 0 1 2 3 4 5 6 7 8 9 a b c d e f 0123456789abcdef 00: 14 00 00 00 00 00 00 00 00 00 41 0e bc 18 01 13 ?.........A????? 10: 25 37 00 00 00 00 38 00 46 62 04 a8 00 00 1c 84 %7....8.Fb??..?? 20: 1c bf 04 a8 1e 70 02 1e 00 00 04 a8 08 12 1b ac ?????p??..?????? 30: 00 00 00 00 00 00 00 00 00 00 00 80 00 00 00 b0 ...........?...? 40: 00 50 f0 76 10 68 68 68 68 00 80 00 00 00 00 00 .P?v?hhhh.?..... 50: 00 00 02 0d 6d 02 00 00 00 00 00 00 00 00 00 00 ..??m?.......... 60: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................ 70: 01 0a 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ??.............. 80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................ 90: 00 00 00 00 c0 00 40 00 03 02 e0 18 30 61 00 00 ....?.@.????0a.. a0: 00 00 a4 a4 08 04 00 00 00 00 00 40 00 00 40 14 ..????.....@..@? b0: 00 00 00 00 00 00 00 00 00 00 10 00 00 00 00 00 ..........?..... c0: 00 00 00 00 00 00 06 00 00 03 00 00 02 00 01 04 ......?..?..?.?? d0: 0c ff 80 80 80 00 00 00 00 00 00 00 00 00 88 01 ?.???.........?? e0: d0 70 01 00 00 00 fd 00 00 00 52 46 00 00 00 00 ?p?...?...RF.... f0: 95 04 ff 00 00 00 00 00 00 00 7d aa 1c 00 b0 00 ??........}??.?. 检测 HDMI 显示器,并在 i.MX8MP 上检索 EDID 数据。HDMI-A -1 是 DSI 转 HDMI 端口,HDMI-A-2 是原生 HDMI 端口。 root@verdin-imx8mp-15288064:/home/torizon# cat /sys/class/drm/card0-HDMI-A-1/edid | edid-decode edid-decode (hex): 00 ff ff ff ff ff ff 00 30 ae 86 10 01 01 01 01 22 15 01 03 80 29 1a 78 ee e5 b5 a3 55 49 99 27 13 50 54 af ef 00 61 40 81 c0 81 80 81 8a 81 90 95 00 95 0f 01 01 64 19 00 40 41 00 26 30 18 88 36 00 a0 1d 00 00 00 18 00 00 00 fc 00 4c 45 4e 20 4c 31 39 35 30 77 44 0a 20 00 00 00 fd 00 32 4c 1e 51 0e 00 0a 20 20 20 20 20 20 00 00 00 ff 00 42 33 34 33 32 38 34 35 0a 20 20 20 20 01 0b 02 03 21 71 4e 06 07 02 03 15 96 11 12 13 04 14 05 1f 90 23 09 07 07 83 01 00 00 65 03 0c 00 10 00 8c 0a d0 90 20 40 31 20 0c 40 55 00 b9 88 21 00 00 18 01 1d 80 18 71 1c 16 20 58 2c 25 00 b9 88 21 00 00 9e 01 1d 80 d0 72 1c 16 20 10 2c 25 80 b9 88 21 00 00 9e 01 1d 00 bc 52 d0 1e 20 b8 28 55 40 b9 88 21 00 00 1e 02 3a 80 d0 72 38 2d 40 10 2c 45 80 b9 88 21 00 00 1e 00 00 00 00 d0   遇到的问题 连接的 HDMI 显示器上没有图像输出 。 dmesg 日志错误:   imx_sec_dsim_drv 32e60000.mipi_dsi: failed to get pmsk for: fin = 12000, fout = 0   故障排除尝试 我们尝试修改设备树中的 MIPI DSI 控制器时钟设置,如下所示: mipi_dsi: mipi_dsi@32e60000 { #address-cells = <1>; #size-cells = <0>; compatible = "fsl,imx8mp-mipi-dsim"; reg = <0x32e60000 0x10000>; clocks = <&media_blk_ctrl IMX8MP_CLK_MEDIA_BLK_CTRL_MIPI_DSI_PCLK>, <&media_blk_ctrl IMX8MP_CLK_MEDIA_BLK_CTRL_MIPI_DSI_CLKREF>; clock-names = "cfg", "pll-ref"; assigned-clocks = <&clk IMX8MP_CLK_MEDIA_MIPI_PHY1_REF>; assigned-clock-parents = <&clk IMX8MP_CLK_24M>; assigned-clock-rates = <11000000>; interrupts = 18 IRQ_TYPE_LEVEL_HIGH>; power-domains = <&mipi_phy1_pd>; status = "disabled"; port@0 { dsim_from_lcdif: endpoint { remote-endpoint = <&lcdif_to_dsim>; }; }; }; 不过,在 dmesg 日志中,默认频率仍显示为 12 MHz 。   要求澄清 我们希望您能就以下几点提供指导: 如何正确更新 fin 和 fout 的值,以解决 pmsk 错误? 要通过 ADV7535 实现正确的图像输出,是否需要对设备树进行任何其他更改? 期待您的见解和建议。 请参阅随附的 dmesg 日志,该话题中的设备树叠加层。 谢谢& , Rupesh Kathar imx8mplus#adv7535 #dsi #hdmi #mipi #i2c #i2s i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: ADV7535: No image output on display 如果您使用的是 5.15,只需将分支更改为 5.15,因为您的源代码是第三方公司的,我不清楚您的驱动程序如何,但请参考 nxp adv7535 驱动程序 linux-imx/drivers/gpu/drm/bridge/adv7511/adv7511_drv.c at lf-5.15.y - nxp-imx/linux-imx - GitHub 并不是所有的分辨率都能支持,有效时钟如下,如果需要新时钟,必须在时钟驱动程序中添加新时钟。 静态常量 int valid_clocks[] = { 148500, 135000, 132000, 108000, 78750, 74250, 65000, 49500, 40000, 31500, }; Re: ADV7535: No image output on display 您好@joanxie, 感谢您对恩智浦内核源代码的指导。 我们已经使我们的设备树与恩智浦内核5.15y(不是你共享的6.12)的imx8mp-evk.dts保持一致,我们的显示器适用于某些分辨率,但不适用于我们的目标分辨率,即1024x768。 除了 adv7535 的设备树外,我们没有做任何其他更改。使用 Toradex 内核 5.15.2.x。 下面的表格列出了哪些方法有效,哪些方法无效。 分辨率 宽高比 标准 常见刷新率 Realtek 显示器 戴尔显示器 640×480 4:3 双向 60 赫兹 工作 工作 800×600 4:3 VESA 60-75 赫兹 工作 工作 1024×768 4:3 VESA 60-75 赫兹 空白/闪烁时 禁用 内部定时发生器 无输出 1280×768 5:3 VESA 60 赫兹 无输出 无输出 1280×720 16:9 双向 24/25/30/50/60 赫兹 工作 工作 1366×768 16:9 VESA 60 赫兹 无输出 无输出 1920×1080p 16:9 双向 24/25/30/50/60 赫兹 工作 工作 只有 1024x768 不工作的可能原因是什么?其他分辨率只需插入 HDMI 即可正常工作。 Re: ADV7535: No image output on display 我之前已经分享过 imx8mp dts 文件,首先,您需要在 dts 中正确设置该桥接器,然后 adv7535 驱动程序就会 https://github.com/nxp-imx/linux-imx/blob/lf-6.12.y/drivers/gpu/drm/bridge/adv7511/adv7511_drv.c Re: ADV7535: No image output on display 嗨 @joanxie, FYR,我们正在使用类似于 Toradex 的 Yavia 载板的定制板。唯一的变化是用 ADV7535 取代了 lontium DSI 转 HDMI 适配器。我们选用 ADV7535,因为恩智浦也在其部分产品中使用该器件。 因此,我们在 Toradex 为 Yavia-WiFi dts 提供的设备树及其父设备树源的基础上进行了设备树修改。 问题中的设备树节点是 1。MIPI-DSI-这里没有修改任何内容(与之前的文章不同,改回了默认值)。其他恩智浦设备也必须使用它。 2。ADV7535 特定的节点和叠加层,我们在上一篇文章中提供了。 驱动程序为sec_mipi_dsim-imx.c,sec-dsim.c,adv7511_drv.c,adv7533.c. 现在,在调整了设备树叠加层之后。我们不再收到 fin、fout 错误。 以下是上述驱动程序的 dev_dbg 日志。 torizon@verdin-imx8mp-15404184:~$ dmesg | grep drm [ 0.000000] Kernel command line: root=LABEL=otaroot rootfstype=ext4 quiet logo.nologo vt.global_cursor_defau lt=0 plymouth.ignore-serial-consoles splash fbcon=map:3 ostree=/ostree/boot.1/torizon/7b778d635701b4e0bbc49652c 421a587ae63ff3c6cbfc07d964084a23df7631d/0 [ 2.771129] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops) [ 2.771181] imx-drm display-subsystem: bound imx-lcdifv3-crtc.1 (ops lcdifv3_crtc_ops) [ 2.772099] imx-drm display-subsystem: bound 32e60000.mipi_dsi (ops imx_sec_dsim_ops [sec_mipi_dsim_imx]) [ 2.772141] imx-drm display-subsystem: bound 32fd8000.hdmi (ops dw_hdmi_imx_ops) [ 2.772468] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 0 [ 2.869610] imx-drm display-subsystem: [drm] fb0: imx-drmdrmfb frame buffer device [ 5.099098] systemd[1]: Starting Load Kernel Module drm... [ 5.188031] systemd[1]: [email protected]: Deactivated successfully. [ 5.188992] systemd[1]: Finished Load Kernel Module drm. [ 5.262319] [drm] Initialized vivante 1.0.0 20170808 for 40000000.mix_gpu_ml on minor 1 torizon@verdin-imx8mp-15404184:~$ dmesg | grep dsim [ 0.000000] Kernel command line: root=LABEL=otaroot rootfstype=ext4 quiet logo.nologo vt.global_cursor_defau lt=0 plymouth.ignore-serial-consoles splash fbcon=map:3 ostree=/ostree/boot.1/torizon/7b778d635701b4e0bbc49652c 421a587ae63ff3c6cbfc07d964084a23df7631d/0 dy [ 2.759952] Kernel module loaded from ramdisk: sec_dsim - result: 0 [ 2.771246] imx_sec_dsim_drv 32e60000.mipi_dsi: sec-dsim bridge bind begin [ 2.771290] imx_sec_dsim_drv 32e60000.mipi_dsi: version number is 0x1060200 [ 2.772085] imx_sec_dsim_drv 32e60000.mipi_dsi: sec-dsim bridge bind end [ 2.772099] imx-drm display-subsystem: bound 32e60000.mipi_dsi (ops imx_sec_dsim_ops [sec_mipi_dsim_imx]) [ 2.916294] Kernel module loaded from ramdisk: sec_mipi_dsim_imx - result: 0 [ 3.259164] imx_sec_dsim_drv 32e60000.mipi_dsi: p: min = 1, max = 6, m: min = 88, max = 1023, s: min = 0, ma x = 5 [ 3.259252] imx_sec_dsim_drv 32e60000.mipi_dsi: fout = 390000, fin = 12000, m = 130, p = 1, s = 2, best_delt a = 0 [ 3.259262] imx_sec_dsim_drv 32e60000.mipi_dsi: no pre-exist hpar can be used [ 18.521539] imx_sec_dsim_drv 32e60000.mipi_dsi: p: min = 1, max = 6, m: min = 88, max = 1023, s: min = 0, ma x = 5 [ 18.521629] imx_sec_dsim_drv 32e60000.mipi_dsi: fout = 390000, fin = 12000, m = 130, p = 1, s = 2, best_delt a = 0 [ 18.521640] imx_sec_dsim_drv 32e60000.mipi_dsi: no pre-exist hpar can be used torizon@verdin-imx8mp-15404184:~$ dmesg | grep adv [ 0.000000] Kernel command line: root=LABEL=otaroot rootfstype=ext4 quiet logo.nologo vt.global_cursor_default=0 plymouth.ignore-serial-consoles splash fbcon=map:3 ostree=/ostree/boot.1/torizon/7b778d635701b4e0bbc49652c421a587ae63ff3c6cbfc07d964084a23df7631d/0 [ 1.052362] adv7511 1-0039: Rev. 20 [ 4.325789] systemd[1]: System time before build time, advancing clock. torizon@verdin-imx8mp-15404184:~$ 有了它,我们还能通过使用 i2cset 直接在 ADV7535 上设置寄存器来生成测试色条图案,这意味着 ADV7535 至 HDMI Sink 显示器的工作正常。问题出在 iMX8MP 与 ADV7535 的通信方式上。 显示屏上仍然没有任何输出。 我们希望了解,恩智浦在其产品中实现 ADV7535 的方式与我们在软件和硬件方法上实现 ADV7535 的方式是否存在差异。 Re: ADV7535: No image output on display 看来这个错误信息是你自己的驱动程序造成的,我在 nxp 驱动程序源代码中没有找到这个信息,而且这个设置也不正确,你无法获得你想要的任何时钟,时钟父频是 24Mhz,如果你设置了 11Mhz,你只能获得 24/2=12Mhz 的时钟、 assigned-clock-parents = <&clk IMX8MP_CLK_24M>; assigned-clock-rates = <11000000>; 你可以参考恩智浦源代码作为参考,检查你关于 lcdif、mipi dsi 和 adv7535 的设置是否正确 linux-imx/arch/arm64/启动/dts/freescale/imx8mp-evk.dts 位于 lf-6.12.y · nxp-imx/linux-imx · GitHub linux-imx/arch/arm64/启动/dts/freescale/imx8mp.dtsi 位于 lf-6.12.y · nxp-imx/linux-imx · GitHub 参考日志,似乎 pll 设置不正确,pll 驱动程序在 linux-imx/drivers/gpu/drm/imx/sec_mipi_pll_1432x.h at lf-6.12.y - nxp-imx/linux-imx - GitHub 您可以仔细检查
View full article
NON XIP via JTAG RT1176 According to this application note: https://www.nxp.com/docs/en/application-note/AN14069.pdf , NON XIP images can only be loaded via MCU Boot Utility via UART and USB.  I was looking to confirm that there is no way to load an XIP Image to flash via MCU Link or Jlink within MCUXpresso IDE?  If MCU Link must be used, I'd like to confirm these are the correct UART pins bellow to route out. I do not see an option for Boot through USB on the datasheet: https://www.nxp.com/docs/en/data-sheet/IMXRT1170AEC.pdf (apologies if I missed it). I've seen a few things online mentioning boot via USB is just connecting USB to the same UART Pins? Thanks, Anteo Re: NON XIP via JTAG RT1176 Hi @AnteoJ , Thanks for your interest in NXP MIMXRT series! Non-XIP images such as those booted from SD card need to be flashed with MCUBootUtility or NXP's official MCUXpresso Secure Provisioning tool. If the image is XIP, it can be programmed to flash by debugger such as JLink/DAP. It's easy to do in MCUXpressoIDE or any other IDE. If you are using RT1170-EVK/EVKB, you will find that there is an MCU-Link on the board, which is an on-board debugger, which is convenient for customers to flash programs and debug directly through the on-board debugger without using an external debugger. Moreover, MCU-Link can be changed to JLink or CMSIS-DAP debugger by programming different firmware. For details, you can check EVK/EVKB hardware schematics. Best regards, Gavin
View full article