Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Customize emWin applications on i.MX RT INTRODUCTION REQUIREMENTS UTILITY USAGE INTEGRATION FUNCTIONAL DEMONSTRATION     1. INTRODUCTION   This document explains how to create an emWin application using as reference the emwin_temperature_control demo included on MCUXpresso SDK, and the emWin Utilities. The custom application for this example, is a Tic-Tac-Toe game, using the emWin GUI as user input, adding the proper logic for game implementation on the emWin generated code, and running on a MIMXRT1060-EVK board. 2. REQUIREMENTS   For the demonstration of this demo, the following material is required: MIMXRT1060-EVK board with the RK043FN02H-CT 4.3" LCD Panel. MCUXpresso IDE v11.0. MCUXpresso SDK v2.6.2 for EVK-MIMXRT1060, including the emWin middleware. Segger emWin 5.38b Libraries and Utilities. emWin 5.30 documentation. 3. UTILITY USAGE   For this demo, just GUIBuilder utility is used, and from this utility, just four widget elements are implemented on the application: Window, Text, Button and Image. At the beginning, one Window is added, configuring its xSize and ySize to 480 x 272, matching with screen's resolution. Over this Window, all the other elements are placed. Each Widget have proprieties that could be added/modified with the right click menu. The overall number of used widgets elements are the following: Three Text widgets, one for the title, other to indicate the next turn, and a third that is empty, because it will be dynamically updated to indicate the winner of the game (or indicating a Draw). Two Image widgets, on where BPM files are loaded and converted to constant arrays, to have the Cross/Circle icons indicating the current turn of the game. Ten Button widgets, one to reinitialize the game, and the other nine to build the 3x3 array used for the game. The complete application layout is shown on the following figure: Then, click on "File->Save" menu, and a file named "WindowDLG.c" file should be created on the same folder on where GUIBuilder utility is located. The "WindowDLG.c" file of this demo, as well as the BMP files for the cross/circle icons could be found on the attachments of this document. Additionally, you could also click on "File->Open" to open the downloaded "WindowDLG.c" file and modify it by your own. 4. INTEGRATION   1) First of all, it is required to import the "emwin_temperature_control" demo included on MCUXpresso SDK for MIMXRT1060-EVK board: Import SDK example(s) -> evkmimxrt1060 -> emwin_examples -> emwin_temperature_control 2) Just after importing the demo, by convenience we have renamed the project and the "source->emwin_temperature_control.c" to "evkmimxrt1060_emwin_tictactoe" and "emwin_tictactoe.c" (right click -> rename). After applying these changes, the demo should be able to be compiled and downloaded without errors and running without issues: 3) Then, open the "WindowDLG.c" file generated by the GUIBuilder and locate the "Defines" section. Copy all of them and replace the Definitions for Widgets IDs already included on the "emwin_tictactoe.c" file. 4) Also remove the "Some dimension defines" and "Colors" sections of the "emwin_tictactoe.c" file, and also the content of "Structures", "Static data". From the same file, also remove the sections for "_aGradient", "_GetSelectedRoom", "_SetFanButtonState", "_cbButton", "_cbButtonFan", "_cbKnob", "_DrawKnob", "_OnRelease". 5) Add the "_acImage_0" and "_acImage_1" arrays from the "WindowDLG.c" file to the "Static data" section of "emwin_tictactoe.c" file. 6) Replace all the elements from the "_aDialogCreate" array from the "emwin_tictactoe.c" with the ones from the "WindowDLG.c" file. 7) Add the function "_GetImageById" and replace the function "_cbDialog" from the "WindowDLG.c" file to the "emwin_tictactoe.c" file. 😎 Until here, the application should be compiled and downloaded without issues, although there is not included any functionality to perform the match. The downloaded layout is shown on the following image: 9) Now, for the implementation of the game itself, the following variables are added to the "Static data" section of "emwin_tictactoe.c" file. "player_turn" indicates who is the current player on move ("X" or "O"). "slots_free" is a counter to know how many remaining slots are free. "winner_player" stores who is the winner, or if the game is a Draw. "slot_status" array is in charge to store the current statusof each slot U8 i, player_turn=0, slots_free=9, winner_player=0; const U32 player_colors[] = {GUI_RED, GUI_BLUE}; enum {SLOT_FREE, SLOT_X, SLOT_O, SLOT_LOCK}; U8 slot_status[] = {SLOT_FREE, SLOT_FREE, SLOT_FREE,                               SLOT_FREE, SLOT_FREE, SLOT_FREE,                               SLOT_FREE, SLOT_FREE, SLOT_FREE}; 10) It was also implemented a function that checks all the possible Slot combinations to define the winner or if the match is a draw. It is the function "CheckWinner" and could be ckeched in the "emwin_tictactoe.c" file of the attachments, that already have all the required changes to have the Tic-Tac-Toe demo running. It is also required adding its function prototype to the "Prototypes" section of "emwin_tictactoe.c" file. 11) Basically, almost all of the game mechanics are defined by the "WM_NOTIFICATION_CLICKED" event of the 9x9 Buttons widgets, so, it is implemented inside the "_cbDialog" function. Below you could find the code for "ID_BUTTON_0"; the red highlights are what change for each Button event:     case ID_BUTTON_0: // Notifications sent by 'Button'       switch(NCode) {       case WM_NOTIFICATION_CLICKED:         // USER START (Optionally insert code for reacting on notification message)         if (slot_status[0] == SLOT_FREE){             hItem = WM_GetDialogItem(pMsg->hWin, ID_BUTTON_0);             BUTTON_SetTextColor(hItem, 0, player_colors[player_turn]);             if (!player_turn){                 BUTTON_SetText(hItem, "X");                 slot_status[0] = SLOT_X;             }             else{                 BUTTON_SetText(hItem, "O");                 slot_status[0] = SLOT_O;             }             player_turn ^= 1;             slots_free--;         }         // USER END         break; 12) For the Restart Button, the implemented logic is in charge of revert back all the Slots status to "Free", erase the content of all the Slots, and also restart the counter of free Slots to nine. 13) After polling all the GUI widgets events, the "CheckWinner" function is called, and then, the winner is defined, indicating it on the "Text_Winner" widget (on the upper-left corner of the screen) that was originally empty. 14) It is also implemented a functionality to directly draw a green rectangle (using emWin Draw functions) around the Cross/Circle icons, depending who is the player on move (also implemented inside the "_cbDialog" function, at the end).   //Draw green rectangle to indicate the player on move   if (!player_turn)   {     GUI_SetColor(GUI_GREEN);     GUI_DrawRoundedFrame(6, 106, 83, 183, 0, 4);     GUI_SetColor(GUI_BLACK);     GUI_DrawRoundedFrame(6, 186, 83, 263, 0, 4);   }   else   {       GUI_SetColor(GUI_GREEN);       GUI_DrawRoundedFrame(6, 186, 83, 263, 0, 4);       GUI_SetColor(GUI_BLACK);       GUI_DrawRoundedFrame(6, 106, 83, 183, 0, 4);   } 15) Finally, a printf with a welcome message was added to "main" function, just before initializing the GUI.     PRINTF("Tic-Tac-Toe demo on i.MXRT1060.\r\n"); 5. FUNCTIONAL DEMONSTRATION   Below are shown captures of the application running, when Cross wins, when Circle wins, and when the match is a draw.  
View full article
MCUXpresso SDK:CI/CD 流水线 概述 在不断发展的嵌入式系统开发领域,支持自动化和高效的工作流程变得越来越重要。本文将探讨如何使用 GitHub Actions、Docker、MCUXpresso SDK 和 Visual Studio Code 为嵌入式项目量身打造一个强大的 CI/CD 管道。通过集成这些工具,开发人员可以自动构建、运行测试,并确保在不同团队和环境中一致地交付固件。 我们首先概述了 CI/CD 在嵌入式工作流程中的优势,包括更快的迭代周期、减少人为错误以及增强协作。接下来,我们深入探讨实际设置:使用 Docker 封装构建环境,利用 GitHub Actions 协调构建和测试,以及在 VS Code 中借助 MCUXpresso SDK 来管理和开发固件项目。真实案例和可重复使用的模板将引导读者创建一个可扩展、可维护且针对基于恩智浦的开发板进行了优化的管道。 无论您是希望实现工作流程现代化的嵌入式工程师,还是希望缩短交付时间的产品经理,本指南都将帮助您在开发生命周期中利用自动化的力量。 前提条件 MCUXpresso for VS Code MCUXpresso SDK 24.12 或更高版本 Git GitHub 帐户 Docker 目录 嵌入式工作流程中的 CI/CD 优势 容器 - Docker 自动化 - GitHub Actions 使用流水线 结束语 1. CI/CD 在嵌入式工作流中的优势 在嵌入式系统开发中实施持续集成和持续部署 (CI/CD) 具有变革性优势,尤其是在使用 MCUXpresso SDK 等复杂工具链和特定硬件限制时。以下是主要优势: 自动构建和测试 CI/CD 管道通过自动编译、链接和闪存流程,消除了手动构建步骤。这可确保每次代码更改都能在一致的构建环境中得到验证,从而降低人为错误的风险,节省宝贵的工程时间。 及早发现问题 通过将自动单元测试、静态分析和在环硬件 (HIL) 测试集成到管道中,开发者可以在错误和回归进入生产硬件前及早发现。这将使固件更加稳定,减少集成过程中的意外情况。 使用 Docker 实现一致的环境 使用 Docker 对构建环境进行容器化,可确保开发机器和 CI 运行程序之间的一致性。开发人员不再需要担心工具链版本不匹配或依赖项缺失的问题,一切都已定义并可重现。 改善协作和代码质量 CI/CD 鼓励频繁提交和拉取请求,这些请求会自动验证。这促进了团队成员间更好的协作,执行编码标准,并确保只有经过测试的代码被合并到主分支中。 更快的迭代和部署 借助自动化管道,固件更新可以快速构建、测试并部署到目标设备或暂存环境中。这加快了开发周期,实现了快速原型开发,尤其适用于敏捷或迭代开发模式。 可追溯性和可审计性 CI/CD 系统会记录每一次构建、测试结果和部署,从而提供清晰的更改历史记录。这对于在汽车或医疗设备等受监管行业中进行调试、确保合规性和维持高质量标准至关重要。 跨项目的可扩展性 管道一旦建立,就可以在多个嵌入式项目中重复使用或调整。这种可扩展性减少了新板或应用程序的设置时间,并促进了团队之间的最佳实践。 2. 容器 - Docker 什么是容器? 容器是轻量级、可移植的软件单元,它将代码与其所有依赖项、库和配置文件组成一个代码包,因此可以在不同的计算环境中可靠地运行。 将容器视为一个独立的盒子,其中包含应用程序运行所需的一切。有几个平台可以用来容器化工作区。本指南将重点介绍 Docker。 Docker是什么? Docker 是一个开源平台,它使开发人员能够在容器中构建、打包和运行应用程序。它简化了创建隔离环境的过程,该环境包括应用程序在不同系统上持续运行所需的代码、库、工具和设置等所有内容。 Docker 的核心是确保开发、测试和部署环境相同,无论您是在本地还是在云中工作,都能帮助解决“它在我的机器上运行”的问题。 使用 Docker 对 MCUXpresso SDK 和构建系统进行容器化的步骤 使用 Docker 对 MCUXpresso SDK 和构建系统进行容器化需要以下组件。 Dockerfile - 这是一个文本文件,其中定义了构建 Docker 镜像的步骤,例如安装软件包、复制文件和设置环境变量。 Docker 镜像 - 这是容器环境的快照。它由 Dockerfile 构建,用于创建容器。 Docker 容器 - Docker 镜像的运行实例。它具有隔离性、轻便性和便携性。 编写 dockerfile 1. 打开文本编辑器(例如 VS Code) 2. 创建一个新的文本文件。将其命名为 dockerfile。将此文件保存为 Docker 文件类型。 3. 创建用于容器化 MCUXpresso SDK 和构建系统的 dockerfile 时,必须指定所需的所有元器件。我们在下面提供了一个模板,你可以复制并粘贴到 dockerfile 中。 该模板的用途: - 使用 Ubuntu 22.04 作为容器的基础。这为构建和运行嵌入式工具提供了稳定的 Linux 环境。 - 防止安装期间出现交互式提示 - 安装使用 MCUXpresso SDK 所需的所有软件包(部分为可选软件包) 安装 ARM GNU 13.2 工具链 - 设置一个工作区,以便使用 West 克隆 MCUXpresso SDK - 配置工具链路径环境变量 # Use Ubuntu 22.04 as the base image FROM ubuntu:22.04 # Set environment variables for non-interactive installations ENV DEBIAN_FRONTEND=noninteractive # Install necessary packages /some optional RUN apt update && apt install -y \ curl \ wget \ ca-certificates \ xz-utils \ libncurses5 \ cmake \ ninja-build \ git \ python3 \ python3-pip \ build-essential \ device-tree-compiler \ unzip \ && rm -rf /var/lib/apt/lists/* # =========================================================================================================== # Notes on flags used: # (-LO) follows http redirects and saves the downloaded file with same name as in URL # (-k) ignores SSL certificate verification. This is needed when system security prevents certain actions # Contact IT to whitelist arm servers if needed. # ============================================================================================================ RUN curl -LO -k https://developer.arm.com/-/media/Files/downloads/gnu/13.2.rel1/binrel/arm-gnu-toolchain-13.2.rel1-x86_64-arm-none-eabi.tar.xz && \ tar xf arm-gnu-toolchain-13.2.rel1-x86_64-arm-none-eabi.tar.xz && \ rm arm-gnu-toolchain-13.2.rel1-x86_64-arm-none-eabi.tar.xz # Install additional Python packages RUN pip3 install --upgrade west imgtool requests # Set the workspace directory WORKDIR /workspace # Clone the mcuxsdk-manifests repository RUN git clone https://github.com/nxp-mcuxpresso/mcuxsdk-manifests.git # Set the MCUXpresso SDK path environment variable ENV MCUX_SDK_PATH=/workspace/mcuxsdk-manifests # Initialize and update the west workspace RUN cd $MCUX_SDK_PATH && \ west init -l . && \ west update # ARMGCC ENV variable ENV ARMGCC_DIR=/arm-gnu-toolchain-13.2.Rel1-x86_64-arm-none-eabi # Default command: Start a shell CMD ["/bin/bash"] 构建容器映像 在继续之前,建议设置一个 GitHub 存储库并配置凭据,以便在后续步骤中使用。 1. 创建一个新的存储库。暂时留空。稍后,它将包含以下项目: .github/workflows/docker-build.yml my_app dockerfile README.md 2. 生成个人访问令牌(PAT)。这将允许您访问 GitHub API。 - 点击“我的”图标 - 选择设置 > 开发者设置 > 个人访问令牌 > 令牌(经典版) - 选择“生成新令牌(经典)” - 范围可以根据您的需求自定义。请在本指南中使用以下范围:delete:packages、repo、write:packages - 点击“生成令牌”。生成令牌后,请务必复制并保存该令牌。 - 然后,将个人访问令牌 (PAT) 存储为 GitHub 密钥。GitHub 密钥将用于工作流文件中的身份验证。这样做是为了在不修改工作流文件的情况下提高可重用性、安全性和轮换性。 - 导航到已创建的存储库,然后单击“设置”。 - 选择密钥和变量,然后单击操作。 - 我们将在此处添加 2 个密钥。一个是用户名,另一个是个人访问令牌。点击“新建存储库密钥”。 用户名的密钥 - 这可以个性化定制。然而,在本指南稍后将介绍的工作流文件中,该变量设置为 GH_USERNAME。将名称设置为 GH_USERNAME。在 “密钥” 字段中输入您的 GitHub 用户名。 令牌的密钥 - 工作流已将变量设置为 GH_PAT。将名称设置为 GH_PAT。在 “密钥” 字段中粘贴您的个人访问令牌。 3. 现在我们可以通过命令行构建容器镜像。 - 克隆存储库的本地副本。打开该位置的命令行界面。 - 将 dockerfile 保存到克隆存储库的根目录下。 登录到 GitHub 容器注册表。运行: echo | docker login ghcr.io -u --password-stdin 输出: -构建容器镜像。这是本指南中最长的步骤,但只需构建一次镜像,就能将其推送到 ghcr 以供使用。运行: docker build -t . 输出: - 要验证您的镜像详细信息,请运行: docker images - 标记 Docker 镜像。此命令不会创建新镜像;它只为现有镜像提供新名称和标签。当你准备将镜像推送到像 GHCR 这样的注册表时尤其有用。Docker 要求在推送镜像前必须标记注册表 URL 和存储库名称。运行: docker tag - 将镜像推送到容器注册表。运行: docker push **注意:由于服务器错误,输出可能显示为失败。如果出现这种情况,只需再次运行该命令即可。 再次运行该命令: 恭喜!MCUXpresso SDK 和构建系统现已集成在容器镜像中,可以用于构建项目。接下来,我们将配置 GitHub 以实现自动化。 3. 自动化 - GitHub Actions 为什么要使用 GitHub Actions? GitHub Actions 是 GitHub 内置的自动化工具,允许你定义工作流,根据推送或拉取请求等事件来构建、测试和部署代码。它使用 YAML 文件来配置这些工作流,从而可以直接在存储库中轻松设置 CI/CD 管道。 1. 在本地克隆您的存储库。然后导航到其根目录。 - 在项目根目录内创建 .github/workflows 目录。 - 导航至 VS 代码并创建一个新文件。将其命名为:docker-build.yml - 我们在下面提供了一个模板,您可以将其复制并粘贴到 docker-build.ymll 中。 该模板的用途: 在推送或 PR 时运行 使用包含 MCUXpresso SDK 工具的容器 检查您的存储库 将您的应用复制到 West 工作区 使用 West 为 FRDM-MCXA153 构建它 name: Build MCUXpresso Project on: push: # branches: [ main ] pull_request: jobs: build: runs-on: ubuntu-latest container: image: ghcr.io/nxp-jose/mcuxpresso-sdk:latest steps: - name: Checkout repository uses: actions/checkout@v3 - name: Copy my_app into west workspace run: | cp -r $GITHUB_WORKSPACE/my_app /workspace/mcuxsdk-manifests/my_app - name: Build project using west working-directory: /workspace/mcuxsdk-manifests run: | echo "Building project..." west build -b frdmmcxa153 my_app 4. 使用管道 完成您的工作区设置 该过程的最后一步是创建一个项目以用于我们的管道。 1. 打开适用于 VS Code 的 MCUXpresso 2. 点击“从存储库导入示例” 3. 从 MCUXpresso SDK 24.12 或更高版本导入一个项目,作为独立示例。将导入位置设置为克隆存储库的根目录。 4. 将更改暂存、提交并推送到您的存储库。现在,您的存储库中应该包含: *注意:如果在本地构建项目,您将看到 .vscode 目录。将此目录推送到存储库是完全可选的。 5. 推送完成后,在 GitHub 上启用工作流。启用工作流后。连续的推送或拉取请求将触发自动项目构建。 6. 检查构建细节。 - 导航至 GitHub 上的“操作”选项卡 - “操作”选项卡将显示工作流已运行的所有实例。 - 点击“构建”查看详细信息。 - 显示的详细信息是构建过程中执行的各个步骤。点击步骤以查看具体详情。 5. 结论 本指南中概述的 CI/CD 管道为使用 Docker、MCUXpresso SDK 和 GitHub Actions 自动构建提供了一个简单而有效的起点。虽然该示例以基本工作流为重点,但可对其进行广泛自定义,以满足项目的特定需求,例如集成自动测试、添加质量检查或使用自定义 MCUXpresso SDK 清单。利用这些工具,团队可以简化开发流程,确保一致性,并以最少的人工干预来扩展流程。 MCUXpresso SDK
View full article
コミュニティガイドライン NXPコミュニティへようこそ  NXPコミュニティ は 、NXPのお客様、パートナー、および従業員が、 組み込み設計のトピック や 技術的な質問 について 、アイデアや ヒントを共有したり、質問 したり、協力 したり、意見を受け取ったりする機会を提供します 。 当社の コミュニティ は 、コミュニケーション、コンテンツ作成、アイデアの共有、問題解決のためのこの包括的なコラボレーション環境を使用して 、お客様が 設計プロセスを迅速かつ効率的に革新 し、進める のを支援します 。 開発者コミュニティから専門家のアドバイスを受けることができます。 NXPサポート チームは 、 これらのフォーラムを監視して回答を提供し、 フィードバック に耳を傾け ます 。誰でもメッセージを読むことができますが、 質問 、体験 、回答 を 投稿できるのは、登録 されたメンバー nxp.com のみです 。   進行状況を追跡する バッジ:バッジは、さまざまな種類の個々の行動や活動についてメンバーを表彰します。多くのバッジは簡単に獲得でき、メンバーが参加を開始するとすぐに授与されます。バッジは、メンバーがコミュニティにもたらす特定のスキルセットを識別するのに役立ちます。  ランク: ランクは 、複数の異なる、しばしば無関係なアクションを完了したメンバーを表彰します。 メンバーは 複数のバッジを取得できますが、 メンバーは 一度に保持できるランクは1つだけです。メンバーのランクは、 コミュニティにおける メンバー の全体的なステータス を示す n 指標 です 。 カテゴリーエキスパート: 誰でもカテゴリーエキスパートになれる ので 、 メンバー は引き続き 参加して他の人を助ける こと を奨励し 。E xperts は、 特定のカテゴリまたはボードへの参加に基づいています 。 重複する投稿を作成する空白:   B 新しい質問やアイデアを投稿する前に 、メンバーにグローバル検索バーを使用して、その質問やアイデアがすでに他のユーザーによって投稿されているかどうかを確認することをお勧めします。 既存の質問やアイデアを見つけた場合は、この投稿にコメントを追加して、同じまたは類似の質問やアイデアがあることをコミュニティメンバーに知らせることをお勧めします。     新しい投稿の作成: 質問やアイデアを投稿するときは、できるだけ多くの情報を提供してください。 投稿の件名に問題を記載する場合は特に注意してください。「助けてください」や「これは機能しません」などの件名は曖昧すぎます。「USBが NXP製品 で動作しない」などの件名 は、問題に精通している人の注意を引き付ける可能性が高くなります。 投稿を追加すべき 適切なフォーラムを特定します 。彼は 、他のメンバーがこの投稿で協力するのを助け ます 。 スマートタグとラベルを 投稿に含めると、検索エンジンで簡単に見つけることができます 。 すべての コラボレーションは他の人を助けることができる ことを忘れないでください 。   投稿が解決した ことを確認する p ost s ha は 、それが解決された場合に表示する機能と 回答へのクイックリンク を持っています 、新しい投稿がある場合は、問題をトラックに追 って、 答えがあなたのものであっても 、 回答 で 返信 をマーク してください。 すべてのコラボレーションは 、バッジとランクに直接反映 されることを忘れないでください。 プロフィール で 進行状況を追跡します 。   Reportの不適切なコンテンツ  コミュニティのメンバーとして、コミュニティを有機的で清潔に保つために、あなたは私たちが協力することができます。  コミュニティに関係のないトピックを投稿または返信している他のユーザーを見つけた場合は、他のユーザーからこれらの不正行為を報告できます。 (報告された不正使用は、NXPサポートチームによって監視されます)。    他のメンバーを尊重し、問題を避けてください  「礼儀正しく、皆さん!」。  コミュニティや機能を悪用することを 禁止 されることを避け てください コミュニティのモデレーターは、コンテンツを継続的にレビューしています 。違反内容にもよりますが 、 当サイトからのストライキ や 永久 追放 は避け てください。 例: 2人のユーザー 間で kudo を 磨く 。   NXPコミュニティでは、このサイトの尊重と良好な使用を保証したいと考えています。  コミュニティ違反の例:  スタッフや他のコミュニティメンバーになりすまそうとする行為  暴力の脅威  ヘイトまたは人種差別的な発言  違法または有害と見なされるJavaScript、アクティブコード、データ、テキスト、ファイル、リンク、ソフトウェア、チャット、通信、またはその他の資料(以下「コンテンツ」)を送信すること  議論の流れを乱すことを目的とした反復的なスレッドやスパム    FAQサイトをご覧ください 
View full article
blhost を使用して LPC54(S)0xx フラッシュをプログラム/消去します 注:このドキュメントでは、フラッシュローダーに関する簡単な説明を提供し、フラッシュローダーの詳細については、 SDK_2.5.0_LPCXpresso54S018\middleware\mcu-boot\doc にある LPC540xxフラッシュローダーユーザーズGuide.pdf 入門を参照してください。 LPC54S0xx SDKをダウンロードします。 フラッシュローダープロジェクトをコンパイルしてflashloader.binを生成します プロジェクトはsdk \ boards \ lpcxpresso54s018 \ bootloader_examples \ flashloaderにあります dfu-util.exe または IDE を使用して、flashloader.bin を RAM にロードします。 dfu-util は http://dfu-util.sourceforge.net/releases/ からダウンロードできます。 ISPピンを構成してから、チップをリセットして、チップをUSB1 DFUブートモードにします。 ブート・モード ISP2の PIO0_6ピン ISP1 PIO0_5ピン ISP0 PIO0_4ピン 形容 USB1 DFUブート LOW LOW HIGH USB DFUクラスは、USB1高速ポートを介してSRAMにイメージをダウンロードするために使用されます。 LPC54S0xxデバイスUSB1高速ポートとPCをUSBで接続します。以下は、flashloader.binをロードするコマンドラインです。 dfu-util.exeドル –D flashloader.bin   blhost を使用して LPC540xxM/LPC54S0xxM フラッシュをプログラム/消去 フラッシュローダバイナリがダウンロードされ、LPC54S0xxプラットフォーム上で実行が開始され、LPC54S0xxプラットフォーム USB1(High-Speed) とホストの間に物理的なUSB接続が残ると、フラッシュローダはコマンドを受信する準備が整います。 blhost -u 0x1fc9,0x01a2 -- プロパティ 12 を取得 blhost -u 0x1fc9,0x01a2 -- メモリいっぱい 0x2000d000 4 0xc0000004 blhost -u 0x1fc9,0x01a2 -- configure-memory 0xa 0x2000d000 blhost -u 0x1fc9,0x01a2 -- プロパティ取得 25 0xa blhost -u 0x1fc9,0x01a2 -t 100000 -- フラッシュ消去領域0x10000000 0x100000 blhost -u 0x1fc9,0x01a2 -t 100000 -- 書き込みメモリ 0x10000000 xxx.bin 注:xxx.bin フラッシュにダウンロードする必要があるターゲットファイルです。 著者: ハオ・リュウ  Hao Liuさん、ありがとうございました。
View full article
LPC177x_8x u-boot端口 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 该项目解释了如何使用 LPC177x_8x 设备为平台构建和部署 u-boot。要构建 u-boot,您需要运行 Linux 操作系统的系统、适用于 Linux 操作系统的最新 CodeSourcery GNU 工具、u-boot 源代码以及适用于 LPC1788 的 u-boot 补丁。 已实现的功能 -------------------------------------------------------------------------------- 支持带有 32 位 DRAM(32MB)的 EA1788 主板 支持EA1788板的NAND FLASH 支持LPC177x_8x内部FLASH 以太网支持 有限的 MPU 支持 u-boot 已知问题 -------------------------------------------------------------------------------- 问题:“重置”命令导致电路板崩溃 解决方法:改用“cmreset”命令 问题:“boot”命令导致主板崩溃 解决方法:使用环境变量和 go 命令编写脚本 问题:bootvx 命令导致主板崩溃 解决方法:无,但没有理由使用此命令 未实现的功能 -------------------------------------------------------------------------------- FLASH“保护”命令和功能未实现(易于实现) 未实现中断/NVIC 支持(易于实现) 可能的改进 -------------------------------------------------------------------------------- Systick 可以代替 LPC1788 匹配定时器 重定位代码已被“绕过”,并且未正确实施 针对设备特定 IRQ 的宏文件,即需要包含弱链接 在启动文件中(特定于架构的设备覆盖) 有一个基本的 MPU 驱动程序,似乎可以工作,但可以改进 以太网驱动程序和 PHY 设置是“特定于板的”,但可以移动 到驱动程序区域,可以使用通用 PHY 支持 u-boot 启动操作概述 -------------------------------------------------------------------------------- 以下是 u-boot 如何在 LPC1788 上启动的概述。 - LPC1788 启动 ROM 将控制权转移到内部 FLASH 中的 u-boot 代码 每个 CM3 启动过程的地址 0x0 - u-boot 代码首先设置 MPU - 引脚复用、时钟和 DRAM 均已初始化 - 代码和数据从 FLASH 迁移到 DRAM - DRAM 中的 BSS 段被清除 - 控制权转移到 DRAM 中的 u-boot 代码 - 调用 u-boot board_init_f() 进行初始 u-boot 设置 - board_init_r() 用于稍后的 u-boot 设置 - u-boot 在 DRAM 之外正常运行 移植文件的位置 -------------------------------------------------------------------------------- arch/arm/cpu/cortex-m3 - Cortex M3 特定文件(mpu、启动等) arch/arm/cpu/cortex-m3/lpc1788 - LPC1788 特定文件(计时器、串行等) arch/arm/include/asm/arch-cortex-m3 - Cortex M3 头文件 arch/arm/include/asm/arch-lpc17xx - LPC177x_8x 特定的头文件 board/nxp - 使用 NXP 设备的电路板专用区域 board/nxp/ea1788 - EA1788 板特定文件(设置、nand 等) include/configs/ea1788.h - EA1788 板特定配置文件
View full article
FTF-ACC-F1247 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 本次会议将涵盖当前变更管理面临的各种主题,包括产品变更通知 (PCN) 对飞思卡尔客户的重要性(特别是在降低成本方面)以及产品和制造流程的质量改进。本次会议还将讨论从金线到铜线转变的几个方面,包括这一转变的技术细节、飞思卡尔为实现这一转变所做的工作、按产品系列进行的推出时间审查以及客户批准的重要性。FTF-ACC-F1247 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 本次会议将涵盖当前变更管理面临的各种主题,包括产品变更通知 (PCN) 对飞思卡尔客户的重要性(特别是在降低成本方面)以及产品和制造流程的质量改进。本次会议还将讨论从金线到铜线转变的几个方面,包括这一转变的技术细节、飞思卡尔为实现这一转变所做的工作、按产品系列进行的推出时间审查以及客户批准的重要性。FTF-ACC-F1247
View full article
i.MX6 上的高保证启动 (HAB) <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 抽象的 安全是我们日常生活中不可避免的一个词。对于我们许多人来说,没有安全性的技术就是没有“信任”的技术。我们都知道,从工作场所到社交聊天,安全在我们的生活中扮演着重要的角色。即使是嵌入式系统也应该实施安全措施,以防止未经授权访问敏感数据。我们如何确保 i.MX6 平台只能使用授权图像启动?让我们来看看名为高保证启动 (HAB) 的酷东西,它使启动映像变得安全而简单。 介绍 数字安全自诞生以来就成为我们生活中不可避免的一部分。对于任何嵌入式系统来说,这种情况都没有什么不同,特别是在处理敏感数据时。许多用于银行交易、国防、医疗、工业和汽车领域的嵌入式设备都严格执行安全规定。 几乎所有嵌入式系统都是根据闪存图像给出的特定指令来工作的。想象一下,如果黑客可以将自己的指令刷入嵌入式设备,那么他就可以完全控制该设备需要执行的操作。如果该设备用于银行目的,那么黑客将获得包括密码在内的所有详细信息!如果该设备用于国防或医疗领域,这种情况会变得更加糟糕。我们如何才能防止这种情况发生?嗯,答案并不那么简单! 嵌入式系统操作系统映像可以从不同的介质(例如 MMC、SD 卡、SATA、以太网等)闪存。由于 SD 卡等介质可以轻松地从一个介质替换到另一个介质,因此在介质上实施安全检查将很困难。此外,人们可以在将操作系统映像刷入这些介质后对其进行更改。因此,仅在刷新图像之前实施安全检查不足以解决这个问题。那么我们如何实施安全检查以确保我们的操作系统映像是安全的?答案是 HAB(高保证靴)。 飞思卡尔在 i.MX6Q 处理器中提供了 HABv4(最新 HAB 版本 4)作为可选功能。HAB 是飞思卡尔安全模块的一部分,可以与 CAAM 和 TrustZone 等其他安全功能协同工作。 使用HAB的优点包括但不限于以下几点: HABv4 实现了启动 ROM 级别的安全性,一旦融合就无法改变。 高效的。 图像控制系统之前的安全检查。 允许多个根密钥。 利用数字签名——保护操作系统映像的最有效方法。 将安全性直接附加到操作系统映像,而不会影响操作系统映像的功能。 通过操作系统映像验证的处理器级别检查可以完全确保安全启动。 HAB 如何运作? HAB基于数字签名的原理。数字签名通过对内容上下文进行签名,使得内容变得安全。该签名过程应包含多种安全算法,以加强最终结果。 HAB 数字签名是 open-ssl 认证、MD5 哈希和 RSA-AES-DES 公钥和私钥检查的组合。 HAB 通过将引导加载程序(u-boot)和操作系统映像(uImage)制作成签名映像来确保安全性。这些签名的图像包含正常的图像内容和安全指令。这些图像也包含公钥和私钥。在HAB过程中,组合得到的公钥哈希码将融合到i.MX6处理器的启动ROM代码中。这种融合使得平台更加安全并且以后无法更改。 在启动过程中,首先启动过程的初始参数应从闪存介质(例如 SD 卡)中获取启动 ROM 代码。然后,HAB 指令将检查启动 ROM 和签名图像中的哈希值。当这两个哈希值匹配时,HAB 进程允许平台启动映像。否则系统将停止所有进程并等待授权图像。 这样,系统就可以防止未经授权的访问,即使有人在后期更改了签名的图像(这最终会改变图像的哈希值,因此在运行时检查期间失败)。 iWave 已成功在我们的i.MX6Q iW-RainboW-G15D-Q7 Linux 平台上实现 HAB,并验证了 HAB 如何保护平台安全。然而,HAB 并非开发平台或模块购买时提供的标准 BSP 的一部分。仅应特殊要求提供。 结论 HAB 是防止未经授权访问操作系统映像的最佳解决方案之一。处理敏感数据(银行、国防等)的嵌入式系统应集成 HAB,以防止外部来源控制整个系统。虽然 HAB 在 i.MX6 平台中是可选功能,但为了确保启动过程更安全,建议集成 HAB。 参考: AN4581_HAB_Application_Note.pdf - 使用 HABv4 在 i.MX50、i.MX53 和 i.MX 6 系列上进行安全启动的应用说明 i.MX_6_Linux_High_Assurance_Boot_(HAB)_User's_Guide.pdf - i.MX 6 Linux 高保证启动 (HAB) 用户指南 概述
View full article
eIQ Neutron NPU Support in Zephyr Zephyr now supports the eIQ Neutron NPU on MCX N and i.MX RT700. This article will describe how to get Zephyr and use the eIQ Neutron NPU libraries and examples.  Some previous experience with eIQ Neutron NPU enablement is assumed, so ensure you're familiar with the eIQ Neutron SDK, converting models for eIQ Neutron NPU, and basic ML concepts by going through the MCX N or i.MX RT700  NPU bare-metal lab guides for VS Code before continuing on below.  Install Software Run the MCUXpresso Installer tool and install three key components: Zephyr Developer Arm GNU Toolchain Zephyr SDK LinkServer Install LinkServer and add LinkServer to the PATH Install VS Code and MCUxpresso VS Code plugin Download Zephyr Open VSCode Go to the MCUXpresso for VSCode plugin and click on Import Repository Go to the Remote tab and select the Zephyr repository. Choose it a directory name and location to download the repository to, and then click on Import. It will take approximately 30 minutes to download the repository. Near the end of the download there will be several prompts in the terminal asking to accept licenses. Type “y” to accept and hit enter. There will be about 10 of these prompts at the end. Open the MCUXpresso Venv Terminal which has a Python virtual environment with all the paths preconfigured that were installed by MCUXpresso Installer. In the terminal that pops up, type “1” to select the default environment. Then navigate to the directory you downloaded Zephyr into Run the following commands to get TensorFlow: west config manifest.project-filter -- +tflite-micro west update Go into the zephyr subdirectory folder cd zephyr Now need to explicitly download the Pull Request (PR) that enables eIQ Neutron. This eventually won’t be necessary when Zephyr 4.5 is released in October, but until then will need to type the following In the command prompt to get it: git remote -v git remote add upstream https://github.com/zephyrproject-rtos/zephyr.git git remote -v   git stash git fetch upstream pull/108834/head:pr-108834 git checkout pr-108834 After this command you should see there’s now a folder at \ \zephyr\samples\boards\nxp\tflm_neutron with example source code. Compile and Run a Zephyr eIQ Neutron NPU example Compile the project with west:  For MCX N: west build -p auto -b frdm_mcxn947/mcxn947/cpu0 samples/boards/nxp/tflm_neutron   For RT700: west build -p auto -b mimxrt700_evk/mimxrt798s/cm33_cpu0 samples/boards/nxp/tflm_neutron Open TeraTerm or other serial terminal program, and connect to the virtual COM port that board enumerated as when you plugged in the USB cable. Use 115200 baud, 1 stop bit, no parity. Flash the resulting code with west flash The serial terminal should show the following: Can debug with west debug  Run your own NPU accelerated ML model in Zephyr Make sure you've gone through the MCX N or i.MX RT700  hands-on labs so you're familiar with the enablement. The same steps for converting a model with the Neutron Compiler tool inside eIQ Neutron SDK, updating the eIQ Neutron libraries, modfiying the operator list, and adding a new model are relevant when using Zephyr, but the file locations will be Zephyr specific. Also note that the header file generated by the Neutron Compiler tool will need to be updated to match the header of the model.hpp file.  Also note that the README.rst file in the Zephyr Neutron example mentions using eIQ Toolkit but that information is outdated and been superseded by eIQ Neutron SDK.  eIQ Neutron example is at \zephyr\samples\boards\nxp\tflm_neutron Neutron libraries are at \modules\hal\nxp\zephyr\blobs\neutron\ Model data is at \zephyr\samples\boards\nxp\tflm_neutron\src\models\mcxn\model.hpp Labels file is at \zephyr\samples\boards\nxp\tflm_neutron\src\labels.h kTensorArenaSize variable is set in \zephyr\samples\boards\nxp\tflm_neutron\src\main_functions.cpp (line 40) and is set to 60KB by default OpResolver is set in \zephyr\samples\boards\nxp\tflm_neutron\src\main_functions.cpp (line 65) The model is selected in \zephyr\samples\boards\nxp\tflm_neutron\src\main_functions.cpp (line 11) Additional References: Blog post on west which Zephyr uses. Zephyr on FRDM-MCXN947 Zephyr on i.MX RT700 Zephyr TensorFlow Hands-On Training
View full article
i.MX RT1064 - PEmicro 连接助手错误和启动配置意外更改 您好, 我正在使用i.MX RT1064控制器,并通过 MCUXpresso IDE 中的PEmicro Multilink接口进行调试/烧录。 有时,我在尝试连接目标设备时会遇到附件中的“PEmicro 连接助手”错误。这个问题似乎是随机发生的;我还没有发现任何特定的软件活动、代码更改或硬件事件会持续触发信号它。 我观察到,当出现此错误时,控制器的启动配置似乎发生了意外变化。在这种状态下,我无法对设备进行刷机或调试。我目前唯一能恢复的方法是将启动配置恢复到其原始设置——内部闪存模式,之后刷写和调试功能就能再次正常工作了。 一些补充细节: MCU:i.MX RT1064 调试探针:PEmicro 多链路通用 Rev E IDE:MCUXpresso IDE 有人遇到过类似的问题吗? 我希望您能就以下方面提供指导: 什么原因会导致启动配置意外更改? 是否存在调试器或应用程序代码可能影响启动配置的已知场景。 防止这种情况发生的建议方法。 能否在不手动更改的情况下通过软件更改启动配置 我附上了错误信息的截图供您参考。 谢谢! i.MX RT106x Re: i.MX RT1064 - PEmicro Connection Assistant Error and Boot Configuration Changing Unexpectedly 你好, 您能帮我解答以下问题吗? 你用的是定制主板还是EVK主板? 您使用的是哪个版本的SDK和IDE? 你烧断过熔丝吗? 您提到需要将启动配置恢复到内部闪存模式——您目前使用的是哪种启动配置? 此致, 巴勃罗 Re: i.MX RT1064 - PEmicro Connection Assistant Error and Boot Configuration Changing Unexpectedly 我使用的是定制电路板,但这个问题在 EVK 上也出现过。 SDK 版本:26.03.00 IDE 版本:25.6.136 我们没有烧断熔丝。 我们通常使用内部启动模式来烧录代码并进行正常操作,但它会随机导致一些意想不到的问题,所以我们将其更改为串行下载模式,擦除闪存,然后再将其改回内部启动模式,之后再次烧录代码。 请查看附件图片以获取启动配置信息。 Re: i.MX RT1064 - PEmicro Connection Assistant Error and Boot Configuration Changing Unexpectedly 你好@Subhasri_S , 通过在 POR_B 的上升沿对 BOOT_MODE0 和 BOOT_MODE1 输入进行采样来初始化 BOOT_MODE 寄存器。对这些输入进行采样后,它们的后续状态不会影响内部 BOOT_MODE 寄存器的内容。 如果 BT_FUSE_SEL = 0,则可以使用 GPIO 引脚而不是 eFuse 来设置特定的启动配置参数。 能否请您在问题出现时,在 RESET 过程中测量一下 BOOT_MODE 和 BT_CFG 引脚的值? 关于此问题的另一种可能结论,请参阅以下知识库文章: 知识库: RT板恢复调试器连接问题 “当闪存中包含异常应用程序(访问内存不存在、内存损坏、时钟配置错误等)时,会导致板处于未知状态,此时调试器无法控制内核。但是,当将核心置于串行下载器模式时,它将使核心处于已知状态,这样,调试器就可以控制核心。 因此,当RT板出现调试器问题时,尝试在串行下载模式下批量擦除外部闪存,这样就能使板载调试器恢复正常状态。 此致, 巴勃罗 Re: i.MX RT1064 - PEmicro Connection Assistant Error and Boot Configuration Changing Unexpectedly 您好,请提供问题发生时记录的 BOOT_MODE 和 BOOT_CFG 引脚值。
View full article
Ara-240 - NVM Memory Compatibility Guide The purpose of this document is to provide extended guidance for selection of compatible Non-Volatile Memory (NVM) devices that are supported by the Ara240 (aka Ara-2) processors. In all cases, it is strongly recommended to follow the memory layout guidelines outlined in the specific SoC requirement documents. Manufacturer Memory Part Number Capacity Renesas NOR SPI FLASH AT25SL321-UUE-T 32Mbit (4MB) ISSI NOR SPI FLASH IS25WJ032F-JTLE-TR 32Mbit (4MB) ISSI NOR SPI FLASH IS25WP032D-JBLE 32Mbit (4MB) Winbond NOR SPI FLASH W25Q16JVSNIQ 16Mbit (2MB) Winbond NOR SPI FLASH W25Q32JWUUIQ 32Mbit (4MB) Winbond NOR SPI FLASH W25Q64JWSSIQ 64Mbit (8MB) XMC NOR SPI FLASH XM25LU64CVIQT 64Mbit (8MB) Note 1: All memory parts are in production unless stated otherwise. Checked June 2026 Re: Ara-240 - NVM Memory Compatibility Guide Cross reference: Ara240 - LPDDR4 Memory Compatibility Guide
View full article
Does the S32K364 support the partial AB_SWAP mode? 你好!我手上有一块客户的S32K364板子,已经安装了AB_SWAP模式的HSE。读取DCMSTAT(0x402AC000)寄存器值为0x00040FF1,按手册代表DCMOTAA_EX这个位有效,芯片处于partial AB_SWAP模式,但是手册中又提到“This AB_SWAP mode is supported only for S32K328, S32K338, S32K348, S32K358, S32K356, S32K336, and S32K388”,请问这是一个doc bug还是什么原因? Re: Does the S32K364 support the partial AB_SWAP mode? Hi@BianHaopeng1 你看错文档了,是 RN00176-for S32K396 HSE 固件 0.2.50.0。 Re: Does the S32K364 support the partial AB_SWAP mode? 对于 S32K394、S32K374 和 S32K364 设备,在 AB-SWAP 启动加载程序期间,0040_0000h 不可用于 IVT,但是 ABSWAP 功能应该是常见功能
View full article
S32G_Howto_Boot_MiniLinux_from_QSPI この記事では、S32Gプラットフォーム上でQSPI Norのみを使用して最小限のLinuxシステムを起動する方法について説明します。主な目的は、Linuxの緊急モード、アップグレードモード、テストモード、または高速起動を有効にすることです。 目次 1. 背景と情報... 2. 1.1 背景情報... 2 1.2 必要書類…2 2. S32G QSPI Norミラーレイアウトの説明... 3. 2.1 S32G Linux BSPによるQSPI Norブートのサポート... 3 2.2 S32G Yocto fsl-image-flashメカニズムの解析... 5 2.3 S32G QSPI Norブートのイメージレイアウトとターゲット変更... 7 3. 画像の変更と編集... 8 3.1 ミラーの変更... 8 3.2 Yoctoコンパイル方法... 10 3.3 スタンドアロンコンパイル方式... 11 4. Linuxカーネルイメージのサイズを縮小する方法... 12 5. 最小限のルートファイルシステムを作成する方法。12 5.1 既存のルートファイルシステムを直接縮小する... 12 5.2 その他の方法... 14 6つのテスト...14 6.1 プログラミング方法...14 6.2 ログを実行します。16 7. ルートファイルシステムにアプリケーションを追加する方法... 17 7.1 Yocto環境にメソッドを追加する... 17 7.2 その他の方法... 17 7.3 テスト結果...17 8. 添付ファイル...17
View full article
RDBESSK358BMU 以太网配置 我目前正在开发恩智浦的 RDBESSK358BMU,该主板有 S32K358 和 GMAC 连接到 Marvell Alaska 88e1510 收发器,还有一个以太网千兆端口(附有硬件方案)。 我想知道,在这种配置下,我是否可以使用带有 lwip_baremetal 示例的 tcpip 协议栈。 使用 Gmac_Loopback 的示例起作用了,但是 lwip_baremetal_example 在 Gmac_initDMA 上失败了,就像我在其他文章中看到的那样,这是一个时钟参考问题,但我正在使用的主板上有外部时钟,所以我不明白如何使这个示例适应我的硬件。有人能提供帮助吗?谢谢!   Re: RDBESSK358BMU Ethernet configuration 你好@gferretts、 是的,我就是这么发现的。你更快 您可以从 RTD 5.0.0 复制缺失的定义: #define DCM_GPR_DCMRWF1_MAC_TX_RMII_CLK_LPBCK_EN_MASK (0x80000000U) #define DCM_GPR_DCMRWF1_MAC_TX_RMII_CLK_LPBCK_EN_SHIFT (31U) #defineDCM_GPR_DCMRWF1_MAC_TX_RMII_CLK_LPBCK_EN_WIDTH (1U) #define DCM_GPR_DCMRWF1_MAC_TX_RMII_CLK_LPBCK_EN(x) (((uint32_t)(((uint32_t)(x)))) << dcm_gpr_dcmrwf1_mac_tx_rmii_clk_lpbck_en_shift)) & dcm_gpr_dcmrwf1_mac_tx_rmii_clk_lpbck_en_mask) ......只是注意到 RTD 的解决方法使用了 |= 关于 Eth_T_InitPhys()--是的,这也是正确的模式--这个例程值得深入检查。 顺祝商祺! 帕维尔 Re: RDBESSK358BMU Ethernet configuration 非常感谢@PavelL!我注意到 GMAC 速度仍为 100 米,因此将其设置为 1G,以匹配 125MHz 时钟,现在它可以在端口 7 上正常 ping 和 TCP echo! 我还注释了"Eth_T_InitPhys();" ,因为我的 PHY 不在 PHY 列表中,它是通过频带配置的。     Re: RDBESSK358BMU Ethernet configuration 你好@PavelL,感谢您的回复。我在使用 lwip 时仍然遇到问题,我也有 s32k3x8evb-q289 但我没有 TJA 子板所以我需要在 S32K358BMU 上测试以太网。 我使用的是"TCPIP STACK 1.0.3 版 RTD3.0.0D2306", 我附上我的 .mex我尝试复制你显示的内容(时钟配置、GMAC 外设和引脚排列)的配置文件和 " 设备.c "用引脚上的 ETH_RESET。 因为我的 RTD 没有环回定义,所以我也尝试手动复制您的 RTD 回转: void device_init(void) { uint16 pitPeriod; /* 为 DCM 模块中的 EMAC 设置 RMII 配置 */ //ip_dcm_gpr->dcmrwf1 = (ip_dcm_gpr->dcmrwf1& ~dcm_gpr_dcmrwf1_emac_conf_sel_mask) | dcm_gpr_dcmrwf1_emac_conf_sel(1u); /* 手动 RTD 转换 */ IP_DCM_GPR->DCMRWF1 = 0x80000040; IP_DCM_GPR->DCMRWF3 = 0x2000; ....}   在这种配置下,示例能够在不超时的情况下实现 Gmac_Ip_InitDMA,并到达主环路,但从我的电脑上 ping 192.168.0.200 结果却是无法连接主机和 ping 超时。 我用示波器验证了 RXC 的存在(当 Phy 协商 100Mbps 时为 25MHz 或 1Gbps 时为 125MHz),因此有一些流量来自 ETH 端口。同时在 TXC 上我现在也能看见 125MHz 但是 TXD0,1 从未被触发。 我希望你们能找到问题所在。   Re: RDBESSK358BMU Ethernet configuration 你好@gferretts、 对于延迟回复,我深表歉意。 遗憾的是,我没有 RD-BESSK358BMU,因此无法为您改编 lwip 示例。总之,我为 S32K358EVB-Q289 和 RGMII 100Mbps 修改了 lwip 示例,没有出现任何问题。让我分享一下我在采用过程中使用的基本步骤(请注意,某些细节可能与 S32K3 RTD / TCPIP 版本有关): 配置工具 - 引脚 采用引脚来适应板的接线 将回转速率设置为最快设置(如适用 应为 RGMII 输出 TX_CLK 配置工具 - 时钟 GMAC 时钟应该是这样的(注意 GMAC 1Gbps:25MHz -> 125MHz;50MHz -> 250MHz)。 配置工具 - GMAC 驱动程序 ETH_MAC_LAYE_TYPE_XGMII, REDUCED, 设置正确的速度 ETH_MAC_LAYER_SPEED_xxx 源代码-设备.c 在 device_init() 的第一行添加 RTD 解决方法 /* 设置 DCM 模块中 GMAC0 的 RGMII 模式配置 */ IP_DCM_GPR->DCMRWF1 |= DCM_GPR_DCMRWF1_MAC_CONF_SEL(0x01) | DCM_GPR_DCMRWF1_MAC_TX_RMII_CLK_LPBCK_EN_MASK; /* 设置 RGMII RX_CLK 直接从 DCM 模块中 GMAC 的 RX_CLK 引脚到达 */ IP_DCM_GPR->DCMRWF3 |= DCM_GPR_DCMRWF3_MAC_RX_CLK_MUX_BYPASS(0x01); 源代码 - test.c 或者,注释掉在一段时间后关闭 TCP/IP 协议栈的部分 这部分比较简单。 从原理图上看,您需要定义 GPIO PTC1 以向 PHY 提供有效的 RESET 脉冲信号,并等待一段时间再初始化 GMAC。PHY 通常在非托管模式下独立工作,只是通过引脚绑扎进行配置。有时,PHY 需要通过 SMI 进行管理。 您使用的是哪个版本的 S32K3 RTD 和哪个版本的 TCP/IP 协议栈? 顺祝商祺! 帕维尔
View full article
iMX95:两路视频输入和两路视频输出。 下午好! 我们有一个想使用 iMX95 的项目,但需要两个视频输入和两个视频输出。在输入方面,我们希望使用两个 MIPI-CSI 输入。关于视频输出,我们希望使用两个 LVDS 输出,因为两个 MIPI-CSI 输入无法使用 MIPI-DSI 输出(由于 MIPI-DSI/CSI 组合)。 我们有几个关于 LVDS 输出的问题,因为我们希望一个输出连接到 LCD(480x272),另一个连接到 LVDS 转 HDMI 桥接器。以下是我们目前提出的问题: 1.输出端是否可以像我们描述的那样?也就是说,一个 LVDS 输出端连接 LCD,另一个 LVDS 输出端连接 LVDS 转 HDMI 桥接器。 2.您推荐哪种 LVDS 转 HDMI 桥接器?我们看到的是 IT6263 芯片,对吗?还有其他人吗? 3.我们需要"LVDS 转 HDMI" 桥接器后的 HDMI 输出支持以下格式:720p50/59/60、1080p50/59/60、PAL、NTSC 和 1080i50/59/60。有可能达到 1080p60 吗?通过 iMX95 的 LVDS 和"LVDS 到 HDMI" 桥接器,是否可以支持隔行扫描格式输出? 谢谢, Daniel。 Re: iMX95: Two video inputs and two video outputs. 感谢您的回复! 关于 HDMI 输出的隔行扫描格式支持...如果我们使用 MIPI-DSI 转 HDMI 桥接器,是否会支持隔行扫描格式,还是会出现与使用 LVDS 转 HDMI 桥接器相同的问题? 谢谢, Daniel。 Re: iMX95: Two video inputs and two video outputs. 你好 1.是的,这是可能的。 2。IT6263 是我们的参考设计中唯一经过测试的芯片,其他 LVDS 转 HDMI 芯片应该可以正常工作。 3. i.MX95 最多支持 2 个 1080p60 LVDS Tx(2x 4 通道或 1x 8 通道),电路板支持包不支持隔行格式,应由您自己实现。 顺祝商祺! Re: iMX95: Two video inputs and two video outputs. 你好 由于我们的 BSP 中未实现隔行格式,因此会出现与使用 LVDS 转 HDMI 桥接器一样的问题。 顺祝商祺! Re: iMX95: Two video inputs and two video outputs. 感谢您的回复! 关于 HDMI 输出的隔行扫描格式支持...如果我们使用 MIPI-DSI 转 HDMI 桥接器,是否会支持隔行扫描格式,还是会出现与使用 LVDS 转 HDMI 桥接器相同的问题? 谢谢, Daniel。 Re: iMX95: Two video inputs and two video outputs. 在澄清了有关产出的问题后(非常感谢),我们想澄清有关两项投入的一些要点。 首先,我会解释我们的想法,然后提出问题。我们要使用 iMX95 的两个 MIPI-CSI 输入:一个连接到 TC358743 芯片,另一个连接到 TC358748 芯片。对于这两种输入,我们希望支持以下格式:720p50/59/60、1080p50/59/60、PAL、NTSC 和 1080i50/59/60。 这一设置提出了以下问题: 1.是否可以像我们描述的那样进行输入?也就是说,一个 MIPI-CSI 输入来自 TC358743,另一个 MIPI-CSI 输入来自 TC358748,这两个输入可支持不同的视频格式。 2.有支持这两种芯片的驱动程序吗?TC358743 和 TC358748? 3.MIPI-CSI 输入是否也支持隔行扫描格式 PAL、NTSC 和 1080i50/59/60?如果是这样,如何使用所谓的"虚拟通道" ?文档似乎支持 MIPI-CSI 输入中的隔行扫描("CSI Pixel Formatter (CSI_PIXEL_FORMATTING)" => " 支持 YUV/RGB 数据类型的隔行扫描模式" ),但我们要求确认。 4.由于 TC358743 芯片的 MIPI-CSI 接口对隔行扫描数据的限制,我们无法使用 YUV422。我们正在考虑使用 YUV444 格式,但通过 MIPI-CSI 接口将其作为 RGB 格式发送,然后可能需要更改软件(驱动程序)。这可能吗?软件(驱动程序等)是否已经准备就绪,还是需要我们自己动手? 5.我们希望将两个 MIPI-CSI 接口之一的输入路由到 H264/HEVC 视频编码器,但该编码器需要 YUV420,而 MIPI-CSI 接口是 YUV422(或 YUV444)。根据文档,似乎可以使用"HW" 模块"CSC 从 YUV422/YUV444/RGB 8 位" 。这个 CSC 是 ISI 模块中的那个,还是另一个?是使用 CSC 进行转换,还是必须通过软件将 YUV422/YUV444 转换为 YUV420? 6.继续前面的问题,考虑将视频解码器输出发送到 LVDS,这需要将 YUV420(解码器)转换为 RGB(LVDS)...这种转换(YUV420 到 RGB)是使用硬件模块(也许可以使用显示控制器的"Blit 控制器" )还是必须在软件中完成? 7.说到色彩转换,我们还有一个关于支持和使用 BT601 和 BT709 的问题。它们是否在任何硬件转换中都受支持,还是取决于特定的系数配置或其他因素? 谢谢, Daniel。 Re: iMX95: Two video inputs and two video outputs. 还有一个新问题: 8.我们需要对 MIPI-CSI 接口的通道数进行动态配置。这可能吗? 谢谢你,丹尼尔。 Re: iMX95: Two video inputs and two video outputs. 谢谢! Re: iMX95: Two video inputs and two video outputs. 你好 关于这些有关输入的新问题,我建议创建一个新的社区主题或提交支持票据。 这将有助于使每个主题集中在一个话题上。 顺祝商祺! Re: iMX95: Two video inputs and two video outputs. 谁能帮我回答最后 8 个问题? 非常感谢, Daniel。 Re: iMX95: Two video inputs and two video outputs. 谢谢!你说得对,我会就这些问题开辟一个新的主题。
View full article
DDR4 calibration issues on LS1046 custom board Good day! We are trying to bring up our custom LS1046-based board up and stucked with DDR4 calibration procedure. SPD data of the modules is red successfully, calibration process starts successfully too, but after that it fails with this reason(log from CodeWarrior 😞  ############################### Run 1 Result for: wrlvl_searcher  ###################################### Test result: [ ============================================================ Updated: WRLVL_CNTL = 0x8655F605, WRLVL_CNTL_2 = 0x00000000, WRLVL_CNTL_3 = 0x00000000, SDRAM_CLK_CNTL = 0x02800000 ============================================================ Updated: WRLVL_CNTL = 0x8655F60A, WRLVL_CNTL_2 = 0x0B0B0C0F, WRLVL_CNTL_3 = 0x0F10110D, SDRAM_CLK_CNTL = 0x02800000 ============================================================ Updated: WRLVL_CNTL = 0x8655F60A, WRLVL_CNTL_2 = 0x0B0B0C0F, WRLVL_CNTL_3 = 0x0F101115, SDRAM_CLK_CNTL = 0x02800000 ============================================================ Updated: WRLVL_CNTL = 0x8655F60A, WRLVL_CNTL_2 = 0x0B0B0C0F, WRLVL_CNTL_3 = 0x0F10111D, SDRAM_CLK_CNTL = 0x02800000 Write Leveling start values are correct and require no further modification, but the test failed due to other issues. Most common failure causes: -incorrect values configured in DDR4 DQn_MAP registers -incorrect ODT values -incorrect driver strength selected -incorrect timing values selected for Timing Configuration 0 properties (TIMING_CFG_0 register) < > {{Write Leveling start values are correct and require no further modification, but the test failed due to other issues.}} Err. capture registers: 0xE20, 0xDEADBEEF 0xE24, 0xDEADBEEF 0xE28, 0x00000000 0xE40, 0x00000000 0xE44, 0x00000000 0xE48, 0x0000001D 0xE4C, 0x60FF2001 0xE50, 0x00001FC0 0xE54, 0x00000000 0xE58, 0x00010000  ############################################ DQ mapping seems to be OK - we have 1:1 mapping from CPU to DDR slot, so we use DQ mappings from DDR module SPD without changing. What can be the problem?  Re: DDR4 calibration issues on LS1046 custom board Is there available RCW on the customer board? Has the ASLEEP led turned on and off? What's the frequency of the DDR clock? Thanks Re: DDR4 calibration issues on LS1046 custom board DDR calibration is performed using a hardcoded RCW. System clock - 100 MHz  DDR bus clock - 800 MHz, DDR data rate - 1600 mt/s Memory module - non-ECC. One interesting thing - from timer to time the 1 st stage of calibration (wrtlvl search) is successfully passed. For example: Test result: [ ================================================= Updated: WRLVL_CNTL = 0x8655F605, WRLVL_CNTL_2 = 0x00000000, WRLVL_CNTL_3 = 0x00000000, SDRAM_CLK_CNTL = 0x02800000 ============================================================ Updated: WRLVL_CNTL = 0x8655F609, WRLVL_CNTL_2 = 0x0A0B0C0E, WRLVL_CNTL_3 = 0x0F10110D, SDRAM_CLK_CNTL = 0x02800000 ============================================================ Updated: WRLVL_CNTL = 0x8655F609, WRLVL_CNTL_2 = 0x0A0B0C0E, WRLVL_CNTL_3 = 0x0F101115, SDRAM_CLK_CNTL = 0x02800000 ============================================================ Updated: WRLVL_CNTL = 0x8655F609, WRLVL_CNTL_2 = 0x0A0B0C0F, WRLVL_CNTL_3 = 0x0F10111D, SDRAM_CLK_CNTL = 0x02800000 < > Err.capture registers: 0xE20, 0x00000000 0xE24, 0x00000000 0xE28,0x00000000 0xE40,0x00000000 0xE44,0x00000000 0xE48, 0x0000001D 0xE4C, 0x00000000 0xE50,0x00000000 0xE54,0x00000000 0xE58, 0x00010000 Dump: 0xF00,0x00000000 0xF04, 0x00000002 0xF08, 0x0000000F 0xF0C,0x14000C20 0xF10, 0x00000000 0xF14, 0x00000000 0xF18, 0x00000000 0xF1C, 0x00000000 0xF20, 0x00000000 0xF24, 0x2F003000 0xF28, 0x32003400 0xF2C, 0x39003B00 0xF30, 0x3C003E00 0xF34, 0x00005000 0xF38, 0x00000000 0xF3C, 0x00000000 0xF40, 0x00000000 0xF44, 0x00000000 0xF48, 0x00000001 0xF4C, 0xD4000000 0xF50, 0x13001500 0xF54, 0x17001900 0xF58, 0x1D001F00 0xF5C, 0x21002200 0xF60, 0x3A000000 0xF64, 0x00009000 0xF68, 0x00000020 0xF6C, 0x00000000 0xF70, 0x0070006F 0xF74, 0x00000000 0xF78, 0x00000000 0xF7C, 0x00000000 0xF80, 0x00000000 0xF84, 0x00000000 0xF88, 0x00000000 0xF8C, 0x00000000 0xF90, 0x00000000 0xF94, 0x80000000 0xF98, 0x00000000 0xF9C, 0x34043104 0xFA0, 0x35043304 0xFA4, 0x31043304 0xFA8, 0x2F043104 0xFAC, 0x04040000 0xFB0, 0x00000003 0xFB4, 0x1F1E1F21 0xFB8, 0x1E1C1F1D 0xFBC, 0x1F1B1D1E 0xFC0, 0x1C1B1C1C 0xFC4, 0x1F1E1F22 0xFC8, 0x1F1F2120 0xFCC, 0x1F1E1F20 0xFD0, 0x1C1D201F 0xFD4, 0x1F1B1B1E 0xFD8, 0x1F1D1E1C 0xFDC, 0x1F1F1D1F 0xFE0, 0x1F1D1E1C 0xFE4, 0x1F1C191A 0xFE8, 0x1C1D1C1A 0xFEC, 0x1F1E1C1E 0xFF0, 0x1E1F1E1A 0xFF4, 0x1F1F1F1F 0xFF8, 0x1F1F1F1F 0xFFC, 0x1F000000 Data: 0x00000009 0x0000000a 0x0000000b 0x0000000c 0x0000000f 0x0000000f 0x00000010 0x00000011 0x0000001d   Just after that I start calibration process again(without any changes in settings) and get a fail: ########## Result for: wrlvl_searcher ######  Test result: [ Updated: WRLVL_CNTL = 0x8655F605, WRLVL_CNTL_2 = 0x00000000, WRLVL_CNTL_3 = 0x00000000, SDRAM_CLK_CNTL = 0x02800000 ============================================================ Updated: WRLVL_CNTL = 0x8655F609, WRLVL_CNTL_2 = 0x0A0B0C0E, WRLVL_CNTL_3 = 0x0F10110D, SDRAM_CLK_CNTL = 0x02800000 ============================================================ Updated: WRLVL_CNTL = 0x8655F609, WRLVL_CNTL_2 = 0x0A0B0C0E, WRLVL_CNTL_3 = 0x0F101115, SDRAM_CLK_CNTL = 0x02800000 ============================================================ Updated: WRLVL_CNTL = 0x8655F609, WRLVL_CNTL_2 = 0x0A0B0C0E, WRLVL_CNTL_3 = 0x0F10111D, SDRAM_CLK_CNTL = 0x02800000 Write Leveling start values are correct and require no further modification, but the test failed due to other issues. Most common failure causes:   - incorrect values configured in DDR4 DQn_MAP registers  - incorrect ODT values  - incorrect driver strength selected  - incorrect timing values selected for Timing Configuration 0 properties (TIMING_CFG_0 register) < > {{Write Leveling start values are correct and require no further modification, but the test failed due to other issues.}} Err. capture registers: 0xE20, 0xDEADBEEF     0xE24, 0xDEADBEEF     0xE28, 0x00000000     0xE40, 0x00000000      0xE44, 0x00000000     0xE48, 0x0000001D     0xE4C, 0x60FF2001     0xE50, 0x00001FC0      0xE54, 0x00000000     0xE58, 0x00010000      Dump: 0xF00, 0x00000000     0xF04, 0x00000002     0xF08, 0x0000000E     0xF0C, 0x14000C20      0xF10, 0x00000000     0xF14, 0x00000000     0xF18, 0x00000000     0xF1C, 0x00000000      0xF20, 0x00000000     0xF24, 0x2F003100     0xF28, 0x33003400     0xF2C, 0x3A003A00      0xF30, 0x3C003E00     0xF34, 0x00005000     0xF38, 0x00000000     0xF3C, 0x00000000      0xF40, 0x00000000     0xF44, 0x00000000     0xF48, 0x00000001     0xF4C, 0xD4000000      0xF50, 0x13001500     0xF54, 0x17001900     0xF58, 0x1D001F00     0xF5C, 0x21002200      0xF60, 0x3A000000     0xF64, 0x00009000     0xF68, 0x00000020     0xF6C, 0x00000000      0xF70, 0x0070006F     0xF74, 0x00000000     0xF78, 0x00000000     0xF7C, 0x00000000      0xF80, 0x00000000     0xF84, 0x00000000     0xF88, 0x00000000     0xF8C, 0x00000000      0xF90, 0x00000000     0xF94, 0x80000000     0xF98, 0x00000000     0xF9C, 0x31022F02      0xFA0, 0x33023102     0xFA4, 0x30023102     0xFA8, 0x2E022F02     0xFAC, 0x02020000      0xFB0, 0x10000003     0xFB4, 0x46444650     0xFB8, 0x45445142     0xFBC, 0x51445052      0xFC0, 0x46454544     0xFC4, 0x45434651     0xFC8, 0x44455045     0xFCC, 0x46455051      0xFD0, 0x45455146     0xFD4, 0x52505052     0xFD8, 0x52505246     0xFDC, 0x50464546      0xFE0, 0x51465042     0xFE4, 0x53464650     0xFE8, 0x52515145     0xFEC, 0x50454546      0xFF0, 0x45505142     0xFF4, 0x46464646     0xFF8, 0x52515350     0xFFC, 0x00000000        Data:  0x00000009 0x0000000a 0x0000000b 0x0000000c 0x0000000e 0x0000000f 0x00000010 0x00000011 0x00000025  ######################################################## Also I' ve noticed that Lane 8 is probed during calibration process, despite to that fact that ddr module is non-ecc and ecc is disabled in project settings.   Re: DDR4 calibration issues on LS1046 custom board 1.The QCVS does not support hardcoded RCW official, valid RCW has to be presented in the RCW source flash or SD card. Would you kindly program the RCW into the flash first, and then do the QCVS DDR validation. 2.Run the command below in the CCS: (bin) 42 % delete all (bin) 43 % config cc cwtap (bin) 44 % show cc (bin) 45 % ccs::config_chain {ls1043a dap sap2} (bin) 46 % display ::ccs::get_config_chain (bin) 47 % ccs::reset_to_debug Send the logs to me. 3.would you kindly share the schematics and confirm the layout follow the AN5097, Hardware and Layout Design Considerations for DDR4 SDRAM Memory Interfaces Thanks Re: DDR4 calibration issues on LS1046 custom board The problem was solved by updating to new version of QCVS(4.27.0)
View full article
RT1040 ADCの問題 IMXRT1040RMに従い、ADC入力信号のGPIOキーパーを無効にします。 ADC 入力 gpio が NC の場合、ADC 読み取り値は異常であり、NC 入力ピンはマルチメーターで測定して 0V になります。 NTC 温度センサにコネクテッドされた別の ADC チャネルがあります。ADC 読み取り値は正常です。 ADC GPIOピン構成をデフォルトに設定すると( IOMUXC_SetPinConfig(ADC_PIN、0x10B0U))、これはキーパー有効をデフォルトで設定し、NC である入力チャネルの ADC 読み取り値はほぼゼロになります。今回は仕事です。 SO、ADC 入力信号の GPIO の Keeper 機能を無効にする必要がありますか? アナログ(ADC、CMP、DAC、オペアンプ) Re: RT1040 ADC issues こんにちは、メイ: モジュールがコネクテッドではない場合、ADC はフローティングになるように設計されています。モジュールはオプションです。 「ECKMIMXRT1040_ADC_12B1MSPS_SAR_POLLING」に従って、GPIO_AD_B1_04 の ADC 入力ピンをキーパー機能が無効に設定されます。 NC ADC 入力ピンは 0V として測定されますが、キーパーが無効になっている場合、ADC 読み取り値は 0.6 または 0.7V になります。 キーパーがデフォルトで有効になっている場合、ADC の読み取り値はほぼ 0V になります。この方法により、ADCの読み取り値をモジュール検出として使用することができます。 では、キーパーを有効にするとどのような副作用があるのでしょうか。 オプション モジュールの自動検出が必要なので、NC である ADC 入力ピンを読み取るにはどうすればよいですか? Re: RT1040 ADC issues こんにちは@Xiao_Liuさん 弊社の製品にご興味をお持ちいただき、またコミュニティをご利用いただき誠にありがとうございます。 ご質問に関してですが、   はい。ADC 入力ピンの場合、キーパー機能を無効にする必要があります。 NXP SDK デモ PIN 設定を参照してください。   ADC チャネルは浮いたままにしないでください。ピンが NC の場合、変換結果は未定義になります。 キーパーを有効にすると、読み取りが安定しているように見えますが、信頼できる解決策ではなく、推奨される解決策でもありません。   お役に立てれば幸いです よろしくお願いいたします。 メイリュー Re: RT1040 ADC issues こんにちは@Xiao_Liuさん 最新情報をありがとうございます。 ADC ピンでキーパーを有効にすることはお勧めしません。キーパーは最後の状態を保持するため、ADC の読み取りが不正確になり、モジュール検出の信頼性が低下する可能性があります。 安定した正確な結果を得るには、ADC が接続されていないときに明確なデフォルト レベルを設定するために外部抵抗を追加することをお勧めします。 よろしくお願いいたします。 メイリュー Re: RT1040 ADC issues こんにちは、メイ わかった。ADC が接続されていない場合は外部プルアップを使用します。 ご協力いただきありがとうございます。 Re: RT1040 ADC issues こんにちは@Xiao_Liuさん 最新情報をありがとうございます。 この投稿があなたの質問への回答である場合は、「解決策として承認」ボタンをクリックしてください。ありがとう! よろしくお願いいたします。 メイリュー
View full article
ベアメタル用のOSタイマーインターフェース Arm 用の S32DS で動作していた古いドライバ モデルには、ベア メタル実装をサポートするタイマー遅延用の API がありました。新しいリアルタイム・ドライバ モデルでは、同等のものが見つかりません。これを実行しようとするとエラーが発生します。添付のスクリーンショットを参照してください。 それを行う方法はありますか? プロジェクトの詳細: MCU: 144ピン構成のS32K148 システムOS: ベアメタル RTD バージョン: 3.0.0 ドライバー構成: 低レベル (非 Autosar)。スクリーンショットを参照してください。 Re: OS Timer interface for bare metal こんにちは@danielmartynek 更新ありがとうございます。これは私が発見したものと一致しています。いくつかフォローアップがあります: 1.SO、リアルタイム・ドライバには OSIf_TimeDelay() に相当するものはないのでしょうか?ドライバー API の他の部分にも同様のギャップが見られ、既存のコードの移植がやや困難になっています。 2. これらの API はすべての MCAL 実装で統一されていますか?言い換えれば、MCAL 準拠を主張する別のベンダーのハードウェアと MCAL 実装を使用する場合、これらすべての API がそのドライバ実装で利用できると期待できますか?(これを逆に読むこともできます。MCAL 準拠を主張する別のベンダーから NXP に移行する場合、NXP ドライバが他のベンダーのドライバが提供するすべての API を提供すると期待できますか?) よろしくお願いいたします。 ドゥルガー・チョードリー Re: OS Timer interface for bare metal こんにちは、 @durga_choudhuryさん、 OsIf.hを参照してください。以下の機能があります: OsIf_Init()、 OsIf_GetCounter()、 OsIf_MicrosToTicks()、 OsIf_GetElapsed()、 BR、ダニエル Re: OS Timer interface for bare metal こんにちは@durga_choudhuryさん、 1. いいえ、そのような関数はありません。個々のドライバは OsIf API を使用します。たとえば、次のようになります。 2. RTD には以下が含まれます。 AUTOSAR MCALドライバ 低レベルのIPレベルドライバ MCAL の最上位層 (AUTOSAR) のみがポータブルです。 たとえば、Adc_Init()。 しかし、OsIf_GetElapsed() は AUTOSAR API ではなく、NXP 固有のものです。 よろしくお願いいたします。 ダニエル
View full article
T4240から間違ったIDCODEを読み取ったため、USB-TAP経由でダウンロードできません T4240 (T4240RDB に類似) をベースにしたボードをデバッグしています。私の問題は、Codewarrior で USB-TAP 経由でコードをダウンロードできないことです。 1.ハードコードされた RCW をテストしたところ、T4240 は電源投入後約 10 ミリ秒以内に RESET_REQ をアサートすることがわかりました。 2. Codewarrior によって「JTAG チェーンを正しく構成できませんでした」というエラー メッセージが表示され、コンソールに表示されるチップ IDCODE は、QorIQ T4240 リファレンス マニュアルに記載されている 0x0022001d ではなく、0x1022001d になります。 3. Codewarrior のコンソールの出力メッセージには、「エラー メッセージ: T4240: トランザクション中に HRESET が発生しました」と表示されました (以下に添付)。 4. 電源とクロックをすべて測定しましたが、問題ないようです。 誰かこの問題を解決するのを手伝ってくれませんか? ---------------------------------------------------------------------------- ccs_open ipaddr = 127.0.0.1 ポート = 41475 タイムアウト = 15 サーバーh = 0 ccs_open; ccs_error = 0 ccs_get_connection_count サーバーh = 0 カウント = 1 ccs_get_connection_count; ccs_error = 0 ccs_available_connections サーバーh = 0 カウント = 1 ccs_available_connections; ccs_error = 0 ccs_available_connections サーバーh = 0 カウント = 1 ccs_available_connections; ccs_error = 0 ccs_cc_バージョン サーバーh = 0 cc = 0 バージョン.メジャー = 1 バージョン.マイナー = 3 ccs_cc_version; ccs_error = 0 ccs_set_timeout サーバーh = 0 タイムアウト = 15 ccs_set_timeout; ccs_error = 0 ccs_available_connections サーバーh = 0 カウント = 1 ccs_available_connections; ccs_error = 0 ccs_config_server サーバーh = 0 cc = 0 サーバー構成 = 0 値 = 4040 ccs_config_server; ccs_error = 0 ccs_config_chain サーバーh = 0 cc = 0 device_list: (サイズ = 1) デバイス[0]:: core_type=テストコア(20) ccs_config_chain; ccs_error = 0 ccs_jtag_ロック サーバーh = 0 cc = 0 ccs_jtag_lock; ccs_error = 0 JTAG診断   プローブ テスト時の始動電力... テスト結果: 合格   IR スキャン テストを開始しています... テスト結果: 合格   バイパス スキャン テストを開始しています... テスト結果: 合格   任意の TAP 状態移動テストを開始しています... テスト結果: 合格   検出されたJTAG IDコード: OK デバイス0 IDコード: 0x1022001D   ccs_jtag_unlock サーバーh = 0 cc = 0 ccs_jtag_unlock; ccs_error = 0 ccs_config_chain サーバーh = 0 cc = 0 device_list: (サイズ = 1) デバイス[0]:: core_type=T4240(206) ccs_config_chain; ccs_error = 39 エラーメッセージ: T4240: トランザクション中に HRESET が発生しました ccs_get_subcore_error サーバーh = 0 cc = 0 エラー = 60 チェーン位置 = 0 ccs_get_subcore_error; ccs_error = 0; 期間=2ミリ秒 ccs_close サーバーh = 0 ccs_close; ccs_error = 0 Re: Wrong IDCODE read from T4240 and cannot download via USB-TAP こんにちは、 CW の問題のスクリーンショットを共有してください。RCW が間違っている可能性があります。RCWは SB_EN ビットが設定されたターゲットにロードされましたか? 他のボードでもこの問題は発生しますか? WCTAP が他のデバイスで正しく動作していることを確認できますか? Re: Wrong IDCODE read from T4240 and cannot download via USB-TAP サポートありがとうございます。スクリーンショットを以下に添付します。ハードコードされた RCW を使用しており、この場合 SB_EN は無効になっています。私は 5 つのボードを持っていますが、すべて同じ問題で動作しています。現時点では、USB-TAP をテストできるリファレンス ボードがありません。 Re: Wrong IDCODE read from T4240 and cannot download via USB-TAP こんにちは、 RCW が有効でないか、JTAG クロック速度が速いことが原因である可能性があります。JTAGクロック速度を下げて試してください。
View full article
i.MX 93 内存兼容性指南 本文档旨在为 i.MX 93 系列处理器所支持的 LPDDR4/4X 内存器件的选型提供扩展指导。在任何情况下,强烈建议遵循特定 SoC 的 NXP 硬件开发者指南中概述的 DRAM 布局准则。 i.MX 93 系列处理器支持不同的封装,每种封装都有其支持的最高 LPDDR4/4X 数据速率。请参考相应的数据手册。 注意:部分 LPDDR4/4X 器件可能不支持低速运行,此外,DQ ODT 可能无法激活,这会影响这些速度下的信号完整性。如果用例中计划采用低速运行,请咨询内存供应商有关内存器件的配置方面及可能的定制,以确保功能正常。 LPDDR4/4X - 最大支持的密度 SoC 最大数据总线宽度 最大密度 假设的内存组织 说明 i.MX 93 (i.MX 93xx) 16 位 16 Gb / (2 GB) 具有 17 行地址 (R0 - R16) 的单排、单通道设备 1, 2, 3   LPDDR4/4X - 已验证的内存列表 验证过程是一个持续的工作——预计该表格会定期更新。 SoC 密度 内存供应商 已验证的内存型号 说明 i.MX 93 16 Gb/ (2 GB) Micron LPDDR4/4x: MT53E1G16D1FW-046 AAT:A  (Z32N) MT53E1G16D1ZW-046 AAT:C (Z42N) 7 4, 8 8 Gb/ (1 GB) Micron LPDDR4/4x: MT53D512M16D1DS-046 AAT (Z11M) 4, 10 16 Gb/ (2 GB) Micron LPDDR4/4x: MT53E1G32D2FW-046 AUT:B (Z42M) 4, 5, 10 8 Gb/ (1 GB) Nanya LPDDR4: NT6AN512M16AV-J1I LPDDR4x: NT6AP512M16BV-J1I 4, 8 4 Gb/(512 MB) Nanya LPDDR4x: NT6AP256M16AV  4, 8 16 Gb/ (2 GB) Kingston LPDDR4: C1612PC2WDGTKR-U 7, 9 8 Gb/ (1 GB) ISSI LPDDR4: IS43LQ16512A-053BLI 4, 8   8 Gb/ (1 GB) CXMT LPDDR4/4x: CXDB4CBAM-EA-M 4, 9 16 Gb/ (2 GB) JSC LPDDR4x: JSL4BAG167ZAMF  4, 8 8 Gb/ (1 GB) JSC LPDDR4x: JSL4B8G168ZAMF-05x  4, 8 4 Gb/(512 MB) JSC LPDDR4x: JSL4A4G168ZAMF-05 4, 8 2Gb / (256 MB) Winbond  LPDDR4x: W66BQ6NBHAGJ 4, 6, 8 8Gb / (1 GB) IM (Intelligent Memory) LPDDR4x: IM8G16L4JCB-046I 4, 11 4Gb / (512 MB) Samsung LPDDR4: K4F4E164HD-THCL 4, 8 8 Gb / (1 GB) AM(Alliance Memory) LPDDR4X: AS4C512M16MD4V-053BIN 4, 8 2Gb / (256 MB) ISSI LPDDR4: IS46LQ16128A-062BSLI 4, 6, 8   注 1: 这些数值纯粹基于 DDR 控制器和 DDR PHY 的 IP 文档、为其集成到 SoC 中所选的实现参数设置、SoC 参考手册以及 JEDEC 标准 JESD209-4B/JESD209-4-1 (LPDDR4/4X)。因此,除非另有说明,否则它们没有经过验证支持,也不能保证内存供应商会提供具有特定密度和 / 或所需内部组织的 SoC。如果客户选择使用最大密度并在预期用例中采用,需自行承担风险。 注 2: 不支持任何密度的字节模式 LPDDR4/4X 器件(内部在两个芯片之间拆分的 x16 通道,每个 x8),因此,这些数值仅适用于具有 x16 内部组织的器件(在 JEDEC 规范中称为 “标准” 器件)。 注 3: 该 SoC 还支持双秩单通道器件,因此,16Gb/2GB 密度也可通过使用具有 16 行地址 (R0 - R15) 的双秩单通道器件来实现。 注 4: 该内存型号未经过完整的 JEDEC 验证,但通过了所有功能测试项目 注意事项 5: 这是一款双通道 x32 器件。由于 i.MX93 仅支持 16 位 LPDDR4/X 数据总线,因此它只能与其中一个通道接口,从而仅能利用该器件一半的密度。如表格中所示 —— 该器件具有 32Gb/4GB 密度,但只能使用 16Gb/2GB。使用双通道器件的其中一个通道没有功能问题,因为在 LPDDR4/4X 中通道是独立的。  注6: 这是一款新的 JEDEC 100 球封装,尺寸为标准 200 球封装的一半。这种 100 球封装具有与 200 球封装相同的性能和功能,并且具有比标准封装更小、更便宜的额外优势。 注释7: 该器件已被制造商停产,并已更新为新的内存型号。  注释8: 该型号处于活跃状态。于 2025 年 6 月审核。 注释 9: 该型号已过时。 注10: 该器件将在 24 年第二季度被制造商停产,且不会更新为新的内存型号。 注释 11: 在 TSA 分析期间发现了 DQ 眼图裕量问题。vTSA 和稳定性测试未发现任何问题。
View full article
KW47(オートモーティブ)またはMCX W72(IoT/インダストリアル)を使用してPCBを初めて正しく構築するための最適な方法 /*** 2025年4月の最新免責事項: - KW47、MCX W72は、KW45とMCX W71からの直接的なデリバティブです。今後の更新に備えて、このページをブックマークしてください。 - この記事は、KW45、K32W148、MCX W71に基づく早期イネーブルメントを目的としていますが、2025年にKW47とMCX W72の範囲を広げた新しいリリースが予定されているため、更新は保留になっています。 --データシート、リファレンスマニュアル、ハードウェア製造ファイルを含め、ほとんどの設計ドキュメントはリクエストに応じて共有--***/ KW47またはMCX W72を使用してPCBを構築するための重要なリンクと、無線性能、低消費電力、無線認証(CE/FCC/IC)に関することすべてについて、把握しておいてください。 KW47製品のNXPウェブページ:https://www.nxp.com/products/KW47 MCXW72製品のNXPウェブページ:https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/mcx-arm-cortex-m/mcx-w-series-microcontrollers/mcx-w72x-secure-and-ultra-low-power-mcus-for-matter-thread-zigbee-and-bluetooth-le:MCX-W72X KW-MCXW-EVKスタートガイドのNXPウェブページKW47/MCXW72のリリースは保留中 KW47-LOCスタートガイドのNXPウェブページKW47/MCXW72のリリースは保留中 MCXW72-LOCスタートガイドのNXPウェブページKW47/MCXW72のリリースは保留中 ハードウェア KW47 MCX W72 EVKボード:暫定版を添付 KW47 LOCチャネルサウンディングボード - 図:暫定版を添付 KW47-MCXW72-EVKハードウェアガイドライン:リクエストに応じて提供 HVQFN48パッケージ仕様:SOT619-17(D) SOT619-17(DD)のリリースは保留中   KW47-MCXW72-EVKユーザーマニュアルKW47/MCXW72のリリースは保留中 最小BoM(添付ファイル) > > KW45 - MCX W71 - KW47 - MCX W72 Minimum BoM Presentation Customers July25.pdf DCDC管理ガイド(AN13831):KW45/K32W148 - パワーマネジメントハードウェア(nxp.com)KW45はKW47に適用可能KW47/MCXW72はリリース待ち デザインインチェックリスト:本記事末尾の添付ファイルを参照 RFマッチング:Sパラメータ(添付ファイル)KW47/MCXW72のリリースは保留中 PCBでのコインセルアプリケーションの処理方法:  AN14664_Coincell_Hardware_recommendation_Rev1.0.pdf  情報: 「RFの動作はPCBレイアウトおよび製造に依存するため、最終製品化されたプラットフォームのRFで期待どおりの認定を確保するには、PCBプロトタイプ(NXPの推奨事項に基づく)を微調整する必要があります。」 EVKで、RF試験のM10モジュールを接続するには、µFLからSMAへのケーブルが推奨されます。 CSH-SGFB-200-UFFR TE Connectivity / Linx Technologies | Mouser France KW47-LOCまたはMCXW72-LOCにSMAを接続するには、専用コネクタTE Connectivity Ltd CONSMA021.062-Gを取り付けるする必要があります。 KW47ハードウェア移植によるKW45: KW47はKW45とのピン間互換性があります。ただし、ハードウェアの観点からは、一部のコンポーネントの値(RFマッチングコンポーネントの値など)を調整する必要があります。 KW4x周辺の他のコンポーネントについては、現在のシリコン検証に基づいた変更は想定されていません。 また、KW47のピンが新機能に対応するよう、新しい多重化が導入されていることにもご注意ください。たとえば、KW47では2番目のFlex CANが対応します。添付ファイルを参照してください 無線 RFレポート: Bluetooth LEアプリケーションK32W148 foとr 802.15.4アプリケーションのKW45/K32W148 RFシステム評価レポート...KW47/MCXW72のリリースは保留中 - オンデマンドで提供     無線共存: Kinetisワイヤレスファミリ製品Bluetooth Low EnergyとWi-Fiアプリケーション(nxp.com)の共存 KW47/MCXW72のリリースは保留中  距離性能:添付ファイルを参照KW47/MCXW72のリリースは保留中 アンテナ: NXP EVKボード内2.4GHz通信デザイン/アプリケーション用小型平面アンテナ チャンネルサウンディングアプリケーション用アンテナ BLEコネクティビティテスト用バイナリファイル:オンデマンドでSDKにて提供 リターンロス(S11)測定: RFマッチング(S11)のリターンロスを測定する方法RFレポート(AN13728)の一部 ロードプル:KW47/MCXW72のリリースは保留中 RF試験用ソフトウェアツール: IoTツールボックス(モバイルアプリケーション) コネクティビティ製品のコネクティビティテストツール (IoT ツールボックスの一部) DTM: HCI_bbをKinetisファミリ製品で使用する方法 - NXPコミュニティ https://community.nxp.com/t5/Wireless-Connectivity-Knowledge/BLE-HCI-Application-to-set-transmitter-... クリスタル 記事 : KW45/K32W1 32MHz & 32kHz Oscilllation margins - NXP CommunityKW47/MCXW72のリリースは保留中 推奨クリスタル付属 低消費電力 Bluetooth LE電力プロファイル推定ツール KW45_WK47_BLE_power_profile_calculator_v1.32.xlsm 低消費電力              AN14554 Kinetis KW47 & MCX W72 Bluetooth LE Power profile analysis release.pdf 802.15.4 Matter & Zigbee 電力プロファイル推定ツール               MCX W7x 802.15.4 Matter ICD SIT LIT & ZED Power profile v0.2.xlsx                 AN MCX W72 802.15.4 Matter and Zigbee Power profile analysis - proposal.pdf CCC チャネルサウンディング BLE パワープロファイル推定ツール               KW47 Digital Key CCC CS Power Estimator tool v0.8.xlsx               AN14628_AN14628_KW47_CCC_CS_Power_Profile_estimator tool_release.pdf Bluetooth ® チャネルサウンディング技術概要 認証 RF事前認証完了 - 完全認証についてははKW47/MCXW72のリリースは保留中  KW47とMCXW72はBluetooth 6.0チャネルサウンディング認定です。
View full article