2300724_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2300724_en-US

2300724_en-US

8CH-DMIC board configuration, flashing and testing on MIMXRT685-EVK

Hi,

I’m trying to run the dmic_multi_channel CM33 demo on EVK-MIMXRT685 with the 8-DMIC array board.

Per the demo documentation, enabling the 8-DMIC board on J31 requires moving several resistors (e.g. R379, R380, R384, R389, R390, R391, R392 to 2–3). After doing this, FlexSPI Octal Flash (U19) becomes inaccessible:
- LinkServer flashing fails
- ROM ISP (blhost) connects, but FLEX-SPI-NOR shows Sector Size = 0 / Page Size = 0
- Flash erase/write is impossible

My questions:
Is this demo expected to run without Octal Flash (RAM-only workflow)?
Is there an official flashing/boot procedure after the resistor changes?
Are all resistor changes required, or can some remain in the default state to keep FlexSPI flash working?
Right now it looks like the required DMIC hardware setup prevents normal flash programming/boot. How can I test and run the demo?

Thanks for any guidance.

MIMXRT685-EVK 8CH-DMIC 

i.MXRT 600Re: 8CH-DMIC board configuration, flashing and testing on MIMXRT685-EVK

Hi @mlkezarev ,

Thank you so much for your interest in our products and for using our community.

Q1:  Is this demo expected to run without Octal Flash (RAM-only workflow)?

A1:   Yes. This demo is designed to run from SRAM only and does not require Octal Flash.

Q2:Is there an official flashing/boot procedure after the resistor changes?

A2: After the resistor changes are applied, the external Flash is physically disconnected.
Therefore, flashing or booting from Flash is not supported in this hardware configuration.

Q3:Are all resistor changes required, or can some remain in the default state to keep FlexSPI flash working?

A3: If you want to enable 8 DMICs, all the specified resistor changes are required.

I have post a pin configuration screenshot for your reference.

mayliu1_0-1769497506571.png

Q4: Right now it looks like the required DMIC hardware setup prevents normal flash programming/boot. How can I test and run the demo?

A4: You can run on SRAM, just like the SDK demo "evkmimxrt685_dmic_multi_channel_cm33"

mayliu1_1-1769497840920.png

Best Regards

MayLiu

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎01-28-2026 04:26 AM
更新者: