[S32N55 B0] XSPI Flash operation leads to bus fault in CRS During the testing of the latest B0 silicon RTD in CRS, a flash operation leads to a bus fault in the following scenario:
1. A read operation of the external flash of sector size 256Kb is triggered in the 1000ms OS task. This request is being processed in the 1000ms task in a continuous loop until the operation is completed.
2. During the processing of read operation in 1000ms task, a higher priority 0.5ms task is cancelling this read operation. The cancellation of this read operation is successful in the higher priority task. But when the context is restored to the 1000ms task where the read operation had been initiated the core gets a bus fault.
The customer put main in while loop until the current job is processed. They can always reproduce this scenario on RDB.
Priority: MEDIUM RTD Re: [S32N55 B0] XSPI Flash operation leads to bus fault in CRS Hello Dan,
Please find the attached .xdm files. Let me know if you can't download. Re: [S32N55 B0] XSPI Flash operation leads to bus fault in CRS Hello Dan,
Thanks for your response.
They configured this parameter to 200ms.
Sorry about that, I have attached them to this comment.
The RTD version is 1.8.0_CD03.
Re: [S32N55 B0] XSPI Flash operation leads to bus fault in CRS Hello @haoyue-yan,
Look like this issue is related to your OS environment instead of RTD driver. 1. Did you enable "Mem MainFunction Period" for using in OS environment? 2. Your images are quite blur, I can't see in details. Could you send images again with bigger size? 3. what is the RTD package version you used?
Best regards,
Dan
View full article