Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
PN7642 PN7642 GPT 是否支持 GPIO 引脚上的硬件输入捕获?如果可以,哪些GPIO可以连接到GPT捕获通道?如果不是,那么对于 125 kHz RFID 处理,推荐的 ASK/FSK 边沿时间戳标记方法是什么? Re: pn7642 你好@AlexPI 希望你一切都好。 通用定时器可能不支持此功能。或许您可以考虑使用 SCTimer/PWM 模块;有关此模块的更多信息,请参阅安全用户手册(需要签署 NDA,并且必须通过安全访问权限 | NXP 半导体申请)。 问候, 爱德华多。
View full article
pn7642 Does PN7642 GPT support hardware Input Capture on GPIO pins? If yes, which GPIOs can be connected to GPT capture channels? If not, what is the recommended method for timestamping ASK/FSK edges for 125 kHz RFID processing? Re: pn7642 Hello @AlexPI Hope you are doing well. General Purpose Timers may not support such feature. Perhaps you could consider the SCTimer/PWM module; more information on this can be found in the secure User Manual (NDA is required, and must be requested through the Secure Access Rights | NXP Semiconductors). Regards, Eduardo.
View full article
pn7220アンテナ電流 こんにちは、libnfc-nxp-rfExt.confやその他の設定ファイルを使ってPN7220のNFCアンテナ電流を設定する方法についてアドバイスいただけますか?我々のテスト結果によると、アンテナ電流が高すぎるため、低減する必要がある。 Re: pn7220 antenna current こんにちは、 @zhangkai さん。 DPCを有効にすることを推奨しますが、DPCを有効にする前に、キャリブレーションを行う必要があります。 Re: pn7220 antenna current こんにちは、 @zhangkai さん、 もし電流を減らす・制限だけが必要な場合は、ここで説明している方法と同じことができます:https://community.nxp.com/t5/NFC-Knowledge-Base/PN7642-Basic-RF-power-limitation-using-DPC/ta-p/2187514  BR トーマ
View full article
S32 デザインスタジオライセンス問題 こんにちは、 最近ノートPCを交換し、新しいマシンにS32 Design Studioを再インストールしました。 しかし、ライセンスアクティベーションのエラーが発生しています。ライセンスが以前のノートPCに紐づいているため、ソフトウェアがアクティベートできません。 NXPライセンスマネージャーを通じて免許証を返却しようとしましたが、免許返却が不可能であるというメッセージが出ました。 古いマシンのライセンスを解除・解放して、新しいノートPCで有効化できるように手伝ってもらえますか?(私のライセンスキーは81B8-B707-440D-FE7Cです。 ご協力ありがとうございました。 dwjang_1-1782784942499.png dwjang_0-1782784925553.png Re: S32 Design Studio License Problem こんにちは、 利用可能なライセンス数が増加しました。
View full article
RDDRONE-BMS772 Development Board Accessories RDDRONE-BMS772开发板配件 I apologize, you didn't understand me. My current research is about battery state estimation, which requires measuring the voltage, current, and temperature data of a real battery. Therefore, I don't need a battery simulator; I need a real battery. So, I need a battery compatible with my development board and a specific model of the corresponding battery charger. Also, are the PEMicro adapter and SEGGER J-Link Mini debugger mentioned in the link necessary hardware for debugging or programming the development board? Can't the development board be directly connected to a computer for debugging and programming? Are these adapters and debuggers available on the market? Furthermore, besides the hardware you mentioned, are there any other necessary hardware components for the development board? If so, please list the detailed accessory categories and their corresponding models. Thank you very much for your detailed answers to these questions. 抱歉,你没理解我的意思,我目前的研究是关于电池状态估计的,需要测量真实电池的电压电流和温度数据,所以我不需要电池模拟器,我需要的是真实的电池,所以我需要适配开发板的电池和对应电池充电器的具体型号;并且那个链接里提到的PEMicro适配器以及SEGGER J-Link Mini调试器是开发板调试或者烧录算法必须的硬件吗?开发板不能直接连接到电脑上进行调试和烧录程序吗?这些适配器和调试器在市面上可以买到吗?还有,开发板除了你提到的这几个硬件之外还有别的必须硬件吗?如果有的话请帮我列出详细的配件类别及其对应的型号;请您详细解答一下这些疑问,万分感谢。 Re: RDDRONE-BMS772 Development Board Accessories RDDRONE-BMS772开发板配件 Dear Fan007, For battery state estimation research, the RDDRONE-BMS772 supports real 3S to 6S Li-ion/LiPo battery packs (6 V to 26 V) and does not require a specific battery model. The selected battery must include a cell-balancing connector.  A charger compatible with the selected battery chemistry and cell count is required. No dedicated BMS communication interface is needed, as the RDDRONE-BMS772 can disconnect the charging path when necessary. For firmware development and debugging, NXP recommends an external SWD debugger such as a PEMicro Universal Multilink or SEGGER J-Link Mini. The RDDRONE-BMS772 does not include an onboard USB debug interface, so an external debugger is necessary. These debuggers are commercially available. For battery characterization and SOC/SOH algorithm development, a programmable electronic load (E-load) is also highly recommended to perform controlled charge/discharge testing.    With Best Regards, Jozef
View full article
pn7220 天线电流 您好,请问如何通过 libnfc-nxp-rfExt.conf 或其他配置文件配置 PN7220 的 NFC 天线电流?我们的测试表明天线电流过高,需要降低。 Re: pn7220 antenna current 你好@zhangkai 建议启用 DPC,但在启用 DPC 之前,需要对其进行校准。 Re: pn7220 antenna current 你好@zhangkai , 如果您只需要降低/限制电流,您可以按照此处描述的方法进行操作: https://community.nxp.com/t5/NFC-Knowledge-Base/PN7642-Basic-RF-power-limitation-using-DPC/ta-p/2187514 BR 托马
View full article
如何在LVGL中流畅地显示相机帧? 您好,我正在使用MIMXRT1176DMAA芯片。该板配备MIPI摄像头和MIPI液晶显示屏,液晶显示屏主要用于显示LVGL GUI。 目前,我希望在屏幕上显示摄像头的图像,同时在摄像头画面上叠加一些 LVGL 标签。我尝试通过 LVGL Canvas 显示相机帧,但这种方法在将相机帧传输到 Canvas 时引入了额外的处理开销,导致 CPU 使用率高和相机画面卡顿。 请问这个问题有解决办法吗?例如,LCDIFV2 的层功能能否用于在不同的层上显示内容?非常感谢您能提供任何建议。 Re: How to smoothly display camera frames in LVGL? 你好@Vinos ,如果这不是秘密,那解决方案是什么? 此致敬礼 Re: How to smoothly display camera frames in LVGL? 已解决。 Re: How to smoothly display camera frames in LVGL? 经过尝试,我发现只有在 LVGL 任务关闭时,相机屏幕才能流畅运行。目前,Layer0 是 GUI,Layer1 是摄像头。当 Layer0 关闭且 Layer1 打开时,我想添加另一个 Layer2。在 Layer3 的中心,应该有一个空心圆,除了弧形部分以外,其余部分都是透明的。 因此,我使用了 ARGB4444 格式,并通过在 LCD 上绘制一个正方形进行了简单的测试(启用 Layer0 并禁用 Layer1;或者禁用 Layer0 并启用 Layer1)。然而,生成的图像并不透明。每当调用 LCDIFV2_SetLayerBlendConfig 函数时,LCD 上的 Layer3 都不会显示图像。但是,如果将此函数注释掉,液晶显示屏将显示预期的非透明图像。 以下是代码,请参考 SDK 中的示例“lcdifv2_embedded_alpha_cm7”。 #define LCD_WIDTH 480 #define LCD_HEIGHT 640 #define CENTER_LAYER 2 #define DEMO_FB0_ADDR ((uint32_t)s_frameBuffer[0]) AT_NONCACHEABLE_SECTION_ALIGN( uint8_t s_frameBuffer[1][LCD_HEIGHT][LCD_WIDTH][2], 32); void DEMO_FillFrameBuffer(void) { uint32_t x, y; for (y = 0; y < LCD_HEIGHT; y++) { for (x = 0; x < LCD_WIDTH; x++) { s_frameBuffer[0][y][x][0] = 0x11; s_frameBuffer[0][y][x][1] = 0x11; } } } void lcd_center_layer_init() { DEMO_FillFrameBuffer(); /* Layer 1: ARGB4444 */ const lcdifv2_buffer_config_t fb1Config = { .strideBytes = (LCD_WIDTH * 2), .pixelFormat = kLCDIFV2_PixelFormatARGB4444, }; const lcdifv2_blend_config_t blend1Config = { .alphaMode = kLCDIFV2_AlphaEmbedded, }; LCDIFV2_SetLayerBufferConfig(LCDIFV2, CENTER_LAYER, &fb1Config); LCDIFV2_SetLayerSize(LCDIFV2, CENTER_LAYER, 240, 240); LCDIFV2_SetLayerOffset(LCDIFV2, CENTER_LAYER, 0, 0); /* comment or not */ LCDIFV2_SetLayerBlendConfig(LCDIFV2, CENTER_LAYER, &blend1Config); LCDIFV2_SetLayerBufferAddr(LCDIFV2, CENTER_LAYER, DEMO_FB0_ADDR); LCDIFV2_EnableLayer(LCDIFV2, CENTER_LAYER, true); LCDIFV2_TriggerLayerShadowLoad(LCDIFV2, CENTER_LAYER); } 我的代码有错误吗?谢谢。 Re: How to smoothly display camera frames in LVGL? @Vinos ,你好! 请查看以下链接: https://github.com/lvgl/lvgl/issues/262我相信这对您的询问会很有帮助。 如果对你有帮助,请告诉我! 埃德温。 Re: How to smoothly display camera frames in LVGL? 谢谢你的建议。我尝试了第二种解决方案,但是在 LVGL 中,背景是白色的,上面有一些标签。实际结果是,除了标签之外,白色背景完全覆盖了相机图像。如何将这些白色背景设置为透明? Re: How to smoothly display camera frames in LVGL? 嗨@Vinos , 我不清楚您打算如何申请这份申请,所以以下是我的建议: 请参考示例“SDK_MIMXRT1170-EVK\boards\evkmimxrt1170\driver_examples\csi\mipi_rgb”。需要将摄像机捕获的视频与 LVGL 的帧缓冲区进行合成。有两种方法可以做到这一点: 1)将相机图像从相机输出缓冲区复制到LVGL的帧缓冲区。虽然可以用 memcpy 实现,但性能会很差,所以我建议改用 DMA。 2) 直接使用另一层 LCDIFv2 作为相机的输出缓冲区,然后 LCDIFv2 硬件在显示屏上合成不同的层而无需复制。 BR, 埃德温。
View full article
在基于 MC9S12X256 16 位处理器的 SCI 系统上实现 I2C MC9S12XS256 微控制器没有专用的 I2C 端口,但是 SCI 子系统能否用于与 I2C 显示器或类似配件通信? Re: implementing I2c on the sci system on an MC9S12X256 16 BIT I2C 无法与 SCI/LIN 直接通信,因为它们的硬件引脚定义不同。 如果必须使用 I2C 通信,则可能需要使用网关来传输协议(例如 MC9S12)。 Re: implementing I2c on the sci system on an MC9S12X256 16 BIT 嗨@fluffyflex , 它只能通过GPIO进行模拟: https://www.nxp.com/docs/en/application-note/AN5264.pdf https://www.nxp.com/docs/en/application-note-software/AN5264SW.zip 此致, 丹尼尔 Re: implementing I2c on the sci system on an MC9S12X256 16 BIT 谢谢你提供的信息!我会利用这些信息来实现模拟I2C。 此致
View full article
Does i.MX95 support LPDDR5X memory? Does i.MX95 support LPDDR5X memory? If MR8[1:0]=01 or MR5 ID is not in your support list How do i.MX95 check supported or not? check MR register? Re: Does i.MX95 support LPDDR5X memory? Thanks for your quickly apply. Re: Does i.MX95 support LPDDR5X memory? As you said "MR8[1:0] = 01 means the device is LPDDR5X-only " MR8[1:0]=00 support LPDDR5, MR8[1:0]=01 support LPDDR5x. So what should MR8[1:0]=?? support LPDDR5 and LPDDR5x ? Re: Does i.MX95 support LPDDR5X memory? Yes, i.MX95 can work with many LPDDR5X devices, but only if those devices also support LPDDR5 backward-compatibility mode. i.MX95 does NOT support LPDDR5X-only devices.  Therefore, checking whether a memory is supported is not simply a matter of looking at MR8[1:0] or MR5 vendor ID alone. MR8[1:0] = 01 means the device is LPDDR5X-only → treat it as not supported for i.MX95, because NXP states LPDDR5X-only devices cannot be used. MR5 manufacturer/device ID is not in NXP’s validated list → it is not validated by NXP , but that alone is not the same as “impossible.” You still need to confirm from the memory datasheet that the part supports LPDDR5 mode and matches the supported density/organization/timing constraints, then validate it in the board design.
View full article
S32DS 3.5 How can I obtain the toolchain classification report for S32DS3.5, including... What about the TI/TD/TCL reports on analysis and use of constraints and known limitations? Re: S32DS 3.5 Hi, lhy These types of documents have security attributes and require an NDA. Please submit a case through the internal support system. https://support.nxp.com BR Joey Re: S32DS 3.5 thank you
View full article
S32 设计工作室许可证问题 您好。 我最近更换了笔记本电脑,并在新电脑上重新安装了S32设计工作室。 但是,我遇到了许可证激活错误——软件无法激活,因为许可证仍然绑定到我之前的笔记本电脑上。 我尝试通过 NXP 许可证管理器退回许可证,但收到一条消息,称许可证无法退回。 请问您能否帮我从旧电脑上停用/释放许可证,以便我可以在新笔记本电脑上激活它?(我的)许可证密钥为 81B8-B707-440D-FE7C) 谢谢你的帮助。 dwjang_1-1782784942499.png dwjang_0-1782784925553.png Re: S32 Design Studio License Problem 你好, 可用许可证数量已增加。
View full article
キーファクタープラグインで画像を作成する際のエラー spsdkとspsdk-pluginsをインストールして、keyfactorプラグインを使ってRT1064用のイメージを作成しました。venvでbuild_image_win.batファイルを起動すると、エラーが発生します。 SPSDKError: SPSDK: シグネチャプロバイダーはconfig type=keyfactorから作成できませんでした;url=... ログファイルに以下のエラーが表示されています。 INFO:spsdk.utils.service_provider:読み込み中プラグイン: spsdk.sp INFO:spsdk.utils.service_provider:キーファクター型のSignatureProviderが見つかりませんでした。 デバッグ:spsdk.apps.utils.utils:SPSDK:シグネチャプロバイダーはconfig type=keyfactorから作成できませんでした。URL 以下に示すように、環境のアクティブな Python エントリ ポイントを検査するテストを実行しました。 "python -c "import importlib.metadata;print([p.namep は に importlib.metadata.entry_points(group='spsdk.sp')]))」テスト結果は良好で、重要な要素はアクティブなPythonエントリポイントにあります。 ビルドバッチファイルとYAMLファイルを添付しました。 この問題をどう解決すればいいですか? Re: Error when building a image using keyfactor plugin こんにちは、 @cleo さん、 プラグインが正常に読み込まれなかったようです。https://github.com/nxp-mcuxpresso/spsdk_plugins/tree/master/keyfactorのガイドに従いましたか? https://github.com/nxp-mcuxpresso/spsdk_pluginsを参照してください。詳細については、こちらをご覧ください。 お役に立てば幸いです。 すてきな一日を、 カン ------------------------------------------------------------------------------- 注記: この投稿があなたの質問への回答になっている場合は、「正解としてマーク」ボタンをクリックしてください。ありがとうございます! - 前回の投稿から7週間Threadをフォローしており、その後の返信は無視しています もし後で関連する質問があれば、新しいThreadを開き、閉じたThreadを参照してください。 -------------------------------------------------------------------------------
View full article
S32 Design Studio License Problem Hello. I recently changed my laptop and reinstalled S32 Design Studio on the new machine. However, I am encountering a license activation error — the software is unable to activate because the license is still bound to my previous laptop. I attempted to return the license through the NXP License Manager, but received a message stating that the license return is not possible. Could you please help me deactivate/release the license from my old machine so that I can activate it on my new laptop?(my license key is 81B8-B707-440D-FE7C) Thank you for your assistance. dwjang_1-1782784942499.png dwjang_0-1782784925553.png Re: S32 Design Studio License Problem Hi,  the number of available licenses has been increased. 
View full article
MC9S12X256 16ビットのSCIシステムでI2Cを実装する MC9S12XS256マイクロコントローラには専用のI2Cポートはありませんが、SCIサブシステムはI2Cディスプレイや類似のアクセサリと通信するために使えますか? Re: implementing I2c on the sci system on an MC9S12X256 16 BIT I2CはSCI/LINとは異なるハードウェアピン定義であるため、直接通信できません。 MC9S12でI2Cが必須の場合、プロトコルを転送するためにゲートウェイを使用する必要があるかもしれません。 Re: implementing I2c on the sci system on an MC9S12X256 16 BIT こんにちは、 @fluffyflex さん。 GPIOを用いてのみエミュレート可能です: https://www.nxp.com/docs/en/application-note/AN5264.pdf https://www.nxp.com/docs/en/application-note-software/AN5264SW.zip よろしくお願いいたします。 ダニエル Re: implementing I2c on the sci system on an MC9S12X256 16 BIT 情報ありがとうございます!それを参考に、I2Cのシミュレーションを組み込んでみます。 よろしくお願いします。
View full article
i.MX95はLPDDR5Xメモリをサポートしていますか? i.MX95はLPDDR5Xメモリをサポートしていますか? もしMR8[1:0]=01またはMR5 IDがサポートリストにない場合 i.MX95がサポートされているかどうかを確認するにはどうすればよいですか?MR登録簿を確認してください。 Re: Does i.MX95 support LPDDR5X memory? 迅速なご応募ありがとうございます。 Re: Does i.MX95 support LPDDR5X memory? あなたが言ったように、「MR8[1:0] = 01 は、デバイスが LPDDR5X 専用であることを意味します」 MR8[1:0]=00はLPDDR5をサポートし、MR8[1:0]=01はLPDDR5xをサポートします。 では、MR8[1:0]=??LPDDR5とLPDDR5xはサポートできますか? Re: Does i.MX95 support LPDDR5X memory? はい、i.MX95は多くのLPDDR5Xデバイスで動作しますが、それらのデバイスがLPDDR5の後方互換性モードをサポートしている場合に限ります。 i.MX95はLPDDR5X専用デバイスをサポートしていません。 したがって、メモリがサポートされているかどうかを確認するには、単にMR8[1:0]やMR5のベンダーIDだけを見るだけでは不十分です。 MR8[1:0] = 01 はデバイスがLPDDR5Xのみであることを意味します NXPはi.MX95では サポートされていない として扱→。NXPはLPDDR5Xのみデバイスは使用できないと明記している。 MR5の製造元/デバイスIDはNXPの検証済みリストに含まれていません。 → それは NXPによる検証は行われていません しかし、それだけでは「不可能」と同じではない。それでも、メモリデータシートで部品がLPDDR5モードをサポートし、対応される密度・組織・タイミングの制約に合致しているかを確認し、基板設計で検証する必要があります。
View full article
Error when building a image using keyfactor plugin I have installed spsdk and spsdk-plugins to build an image for RT1064 using the keyfactor plugin. When I am launching in venv the build_image_win.bat file I keep getting an error  SPSDKError: SPSDK: Signature provider could not be created from config type=keyfactor;url=... The log file shows the below error. INFO:spsdk.utils.service_provider:Loading plugins: spsdk.sp INFO:spsdk.utils.service_provider:SignatureProvider of type keyfactor was not found. DEBUG:spsdk.apps.utils.utils:SPSDK: Signature provider could not be created from config type=keyfactor;url I ran a test to  inspect the environment's active Python entry points as shown below "python -c "import importlib.metadata; print([p.name for p in importlib.metadata.entry_points(group='spsdk.sp')])"  " and the result of the test is good, keyfactor is in the active Python entry points. I have attached the build batch file and the yaml file. How can I fix this issue? Re: Error when building a image using keyfactor plugin Hi @cleo , Looks like the plugin was not loaded successfully. Did you follow the guide from  https://github.com/nxp-mcuxpresso/spsdk_plugins/tree/master/keyfactor ?  Please refer to https://github.com/nxp-mcuxpresso/spsdk_plugins for more details. Hope that helps, Have a great day, Kan ------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "Mark Correct" button. Thank you! - We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. -------------------------------------------------------------------------------
View full article
How to smoothly display camera frames in LVGL? Hello, I am using the MIMXRT1176DMAA chip. The board is equipped with a MIPI camera and a MIPI LCD, and the LCD primarily used for displaying LVGL GUI. Currently, I would like to display the camera's images on the screen while overlaying some LVGL labels on top of the camera feed. I have attempted to display the camera frames through an LVGL Canvas, but this approach introduced additional processing overhead in transferring camera frames to the Canvas, resulting in high CPU usage and choppy camera feed. Could you please advise if there is a solution to this issue? For instance, can the Layer feature of LCDIFV2 be utilized to display content on different layers? I would greatly appreciate any suggestions you could provide. Re: How to smoothly display camera frames in LVGL? Hello @Vinos , what was the solution if it's not a secret? Kind regards Re: How to smoothly display camera frames in LVGL? Solved. Re: How to smoothly display camera frames in LVGL? After trying, I found that the camera screen only works smoothly when the LVGL task is closed. Currently, Layer0 is the GUI and Layer1 is the camera. I would like to add another Layer2 when Layer0 is closed and Layer1 is opened. In the center of Layer3, there should be a hollow circle with transparency in all parts except for the arc. Therefore, I used the ARGB4444 format and performed a simple test by drawing a square on the LCD(Layer0 enable and Layer1 disable;or Layer0 disable and Layer1 enable). However, the resulting image was not transparent. Whenever the LCDIFV2_SetLayerBlendConfig function is called, there is no image on Layer3 on the LCD. However, if this function is commented out, the LCD displays the expected non-transparent image. Below is the code,reference the example " lcdifv2_embedded_alpha_cm7" in SDK #define LCD_WIDTH 480 #define LCD_HEIGHT 640 #define CENTER_LAYER 2 #define DEMO_FB0_ADDR ((uint32_t)s_frameBuffer[0]) AT_NONCACHEABLE_SECTION_ALIGN( uint8_t s_frameBuffer[1][LCD_HEIGHT][LCD_WIDTH][2], 32); void DEMO_FillFrameBuffer(void) { uint32_t x, y; for (y = 0; y < LCD_HEIGHT; y++) { for (x = 0; x < LCD_WIDTH; x++) { s_frameBuffer[0][y][x][0] = 0x11; s_frameBuffer[0][y][x][1] = 0x11; } } } void lcd_center_layer_init() { DEMO_FillFrameBuffer(); /* Layer 1: ARGB4444 */ const lcdifv2_buffer_config_t fb1Config = { .strideBytes = (LCD_WIDTH * 2), .pixelFormat = kLCDIFV2_PixelFormatARGB4444, }; const lcdifv2_blend_config_t blend1Config = { .alphaMode = kLCDIFV2_AlphaEmbedded, }; LCDIFV2_SetLayerBufferConfig(LCDIFV2, CENTER_LAYER, &fb1Config); LCDIFV2_SetLayerSize(LCDIFV2, CENTER_LAYER, 240, 240); LCDIFV2_SetLayerOffset(LCDIFV2, CENTER_LAYER, 0, 0); /* comment or not */ LCDIFV2_SetLayerBlendConfig(LCDIFV2, CENTER_LAYER, &blend1Config); LCDIFV2_SetLayerBufferAddr(LCDIFV2, CENTER_LAYER, DEMO_FB0_ADDR); LCDIFV2_EnableLayer(LCDIFV2, CENTER_LAYER, true); LCDIFV2_TriggerLayerShadowLoad(LCDIFV2, CENTER_LAYER); } Is there any error in my code? Thank you. Re: How to smoothly display camera frames in LVGL? Hi again @Vinos, Please look into the following link: https://github.com/lvgl/lvgl/issues/262 I believe it will prove very useful for your inquiry. Let me know if it helps! Edwin. Re: How to smoothly display camera frames in LVGL? Thank you for your suggestion. I have tried the second solution, but in LVGL, the general background is white and there are some labels on top. The actual result is that the white background completely covers the camera image except for the labels. How can I make these white backgrounds transparent? Re: How to smoothly display camera frames in LVGL? Hi @Vinos, I am not aware of how you are approaching this application, so here is my recommendation on how to do so: Refer to the example "SDK_MIMXRT1170-EVK\boards\evkmimxrt1170\driver_examples\csi\mipi_rgb". The captured video from camera needs to be composited with framebuffer of LVGL. There are two methods to do this: 1) Copying the camera image from camera output buffer to framebuffer of LVGL. This can be done with memcpy but it will result in bad performance, so I'd recommend using DMA instead. 2) Using another layer of LCDIFv2 as output buffer of camera directly, then LCDIFv2 h/w composites different layers on display without copy. BR, Edwin.
View full article
使用 keyfactor 插件构建镜像时出错 我已经安装了 spsdk 和 spsdk-plugins,以便使用 keyfactor 插件为 RT1064 构建镜像。当我在虚拟环境中运行 build_image_win.bat 文件时,一直出现错误。 SPSDK错误:SPSDK:无法根据配置 type=keyfactor;url=... 创建签名提供程序 日志文件显示以下错误。 信息:spsdk.utils.service_provider:正在加载插件:spsdk.sp INFO:spsdk.utils.service_provider:未找到类型为 keyfactor 的 SignatureProvider。 调试:spsdk.apps.utils.utils:SPSDK:无法根据配置 type=keyfactor;url 创建签名提供程序 我运行了一个测试来检查环境中活动的 Python 入口点,如下所示。 "python -c "import importlib.metadata;print([p.namefor p in importlib.metadata.entry_points(group='spsdk.sp')])"测试结果良好,关键因素在于活跃的 Python 入口点。 我已附上版本批处理文件和 yaml 文件。 我该如何解决这个问题? Re: Error when building a image using keyfactor plugin 嗨@cleo , 插件似乎加载失败。您是否按照https://github.com/nxp-mcuxpresso/spsdk_plugins/tree/master/keyfactor中的指南操作?请参考https://github.com/nxp-mcuxpresso/spsdk_plugins更多详情请见下文。 希望对您有所帮助。 祝你有美好的一天, 坎 ------------------------------------------------------------------------------- 笔记: - 如果此回复解答了您的问题,请点击“标记为正确答案”按钮。谢谢你! - 我们会持续关注帖子,从最后一条回复发出后持续7周,之后的回复将被忽略。 如果您之后有相关问题,请另开新帖并引用已关闭的帖子。 -------------------------------------------------------------------------------
View full article
MCXC242VFM vs MCXC244VFM pinout differences Hello there, I'm designing a board with the MCXC242VFM chip, but I wanted to make it pin to pin compatible with the MCXC244VFM in case I need more FLASH and RAM. From the MCUXpresso Config Tool I see that there's a few pins that differ between MCXC242VFM and MCXC244VFM, but I cannot find any documentation that explains in detail the difference of pinouts.; only thing I can find online on NXP website is that from the product selection tool the MCXC242VFM is reported to have no I2S and 24 GPIOs, while the MCXC244VFM has 1 I2S and 23 GPIOs. For my project I'm not interested in the I2S. Can someone please point me to a document that clearly states the differences of pinout and pins assignment between these two chips? Kind regards, Michele Perla Board Design MCXC Package and IO|GPIO Re: MCXC242VFM vs MCXC244VFM pinout differences Hi @MichelePerla  The MCXC242VFM and MCXC244VFM are both available in the 32-QFN package, but they should not be assumed to be fully pin-to-pin compatible. Please compare the pin assignment tables in the MCX C24X and MCX C44X reference manual. In particular, several pins differ between the two devices. For example, pin 5 is USB_VDD on MCXC242VFM but VOUT33 on MCXC244VFM; pin 6 is PTE16 on MCXC242VFM but VREGIN on MCXC244VFM; and pin 9 also has different analog/reference-related definitions. Therefore, if the board is intended to support both devices, these pins must be reviewed carefully in the schematic and PCB design. MCXC242 RM: MCX C24X Sub-Family Reference Manual Alice_Yang_2-1783650917873.png MCXC244 RM: MCX C44X Sub-Family Reference Manual Alice_Yang_0-1783650899990.png Hope it helps. BR Alice
View full article
MCXC242VFM 与 MCXC244VFM 引脚排列差异 你好呀, 我正在设计一款采用 MCXC242VFM 芯片的电路板,但我希望它能与 MCXC244VFM 引脚兼容,以防我需要更大的 FLASH 和 RAM。 从 MCUXpresso 配置工具中,我发现 MCXC242VFM 和 MCXC244VFM 之间有一些引脚不同,但我找不到任何文档详细解释引脚排列的差异。我在 NXP 网站上唯一能找到的信息是,根据产品选择工具显示,MCXC242VFM 没有 I2S 接口,有 24 个 GPIO 接口,而 MCXC244VFM 有 1 个 I2S 接口和 23 个 GPIO 接口。我的项目对 I2S 不感兴趣。 请问谁能提供一份文档,清楚地说明这两款芯片的引脚排列和引脚分配的区别? 此致敬礼, 米歇尔·佩拉 电路板设计 MCXC 代码包,软件包和 I/O|GPIO Re: MCXC242VFM vs MCXC244VFM pinout differences 嗨@MichelePerla MCXC242VFM 和 MCXC244VFM 均采用 32-QFN 封装,但不应假定它们引脚完全兼容。请比较 MCX C24X 和 MCX C44X 参考手册中的引脚分配表。 具体来说,这两个设备有几个引脚不同。例如,MCXC242VFM 的引脚 5 为 USB_VDD,而 MCXC244VFM 的引脚 5 为 VOUT33;MCXC242VFM 的引脚 6 为 PTE16,而 MCXC244VFM 的引脚 6 为 VREGIN;引脚 9 的模拟/参考相关定义也不同。因此,如果板要支持这两个设备,则必须在原理图和 PCB 设计中仔细检查这些引脚。 MCXC242 RM: MCX C24X 子系列参考手册 Alice_Yang_2-1783650917873.png MCXC244 RM: MCX C44X 子系列参考手册 Alice_Yang_0-1783650899990.png 希望对您有所帮助。 BR 爱丽丝
View full article