2392782_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2392782_en-US

2392782_en-US

Does i.MX95 support LPDDR5X memory?

Does i.MX95 support LPDDR5X memory?

If MR8[1:0]=01 or MR5 ID is not in your support list

How do i.MX95 check supported or not? check MR register?

Re: Does i.MX95 support LPDDR5X memory?

Thanks for your quickly apply.

Re: Does i.MX95 support LPDDR5X memory?

As you said "MR8[1:0] = 01 means the device is LPDDR5X-only "

MR8[1:0]=00 support LPDDR5, MR8[1:0]=01 support LPDDR5x.

So what should MR8[1:0]=?? support LPDDR5 and LPDDR5x ?

Re: Does i.MX95 support LPDDR5X memory?
  • Yes, i.MX95 can work with many LPDDR5X devices, but only if those devices also support LPDDR5 backward-compatibility mode.
  • i.MX95 does NOT support LPDDR5X-only devices. 
  • Therefore, checking whether a memory is supported is not simply a matter of looking at MR8[1:0] or MR5 vendor ID alone.
  • MR8[1:0] = 01 means the device is LPDDR5X-only → treat it as not supported for i.MX95, because NXP states LPDDR5X-only devices cannot be used.
  • MR5 manufacturer/device ID is not in NXP’s validated list → it is not validated by NXP , but that alone is not the same as “impossible.” You still need to confirm from the memory datasheet that the part supports LPDDR5 mode and matches the supported density/organization/timing constraints, then validate it in the board design.
タグ(1)
評価なし
バージョン履歴
最終更新日:
‎07-10-2026 02:28 AM
更新者: