2393285_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2393285_en-US

2393285_en-US

Error when building a image using keyfactor plugin

I have installed spsdk and spsdk-plugins to build an image for RT1064 using the keyfactor plugin. When I am launching in venv the build_image_win.bat file I keep getting an error 

SPSDKError: SPSDK: Signature provider could not be created from config type=keyfactor;url=...

The log file shows the below error.

INFO:spsdk.utils.service_provider:Loading plugins: spsdk.sp
INFO:spsdk.utils.service_provider:SignatureProvider of type keyfactor was not found.
DEBUG:spsdk.apps.utils.utils:SPSDK: Signature provider could not be created from config type=keyfactor;url

I ran a test to  inspect the environment's active Python entry points as shown below
"python -c "import importlib.metadata; print([p.name for p in importlib.metadata.entry_points(group='spsdk.sp')])"  " and the result of the test is good, keyfactor is in the active Python entry points.

I have attached the build batch file and the yaml file.
How can I fix this issue?



Re: Error when building a image using keyfactor plugin

Hi @cleo ,


Looks like the plugin was not loaded successfully. Did you follow the guide from  https://github.com/nxp-mcuxpresso/spsdk_plugins/tree/master/keyfactor ?  Please refer to https://github.com/nxp-mcuxpresso/spsdk_plugins for more details.


Hope that helps,


Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎07-10-2026 02:28 AM
更新者: