2392799_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2392799_en-US

2392799_en-US

RDDRONE-BMS772 Development Board Accessories RDDRONE-BMS772开发板配件

I apologize, you didn't understand me. My current research is about battery state estimation, which requires measuring the voltage, current, and temperature data of a real battery. Therefore, I don't need a battery simulator; I need a real battery. So, I need a battery compatible with my development board and a specific model of the corresponding battery charger. Also, are the PEMicro adapter and SEGGER J-Link Mini debugger mentioned in the link necessary hardware for debugging or programming the development board? Can't the development board be directly connected to a computer for debugging and programming? Are these adapters and debuggers available on the market? Furthermore, besides the hardware you mentioned, are there any other necessary hardware components for the development board? If so, please list the detailed accessory categories and their corresponding models. Thank you very much for your detailed answers to these questions.



抱歉,你没理解我的意思,我目前的研究是关于电池状态估计的,需要测量真实电池的电压电流和温度数据,所以我不需要电池模拟器,我需要的是真实的电池,所以我需要适配开发板的电池和对应电池充电器的具体型号;并且那个链接里提到的PEMicro适配器以及SEGGER J-Link Mini调试器是开发板调试或者烧录算法必须的硬件吗?开发板不能直接连接到电脑上进行调试和烧录程序吗?这些适配器和调试器在市面上可以买到吗?还有,开发板除了你提到的这几个硬件之外还有别的必须硬件吗?如果有的话请帮我列出详细的配件类别及其对应的型号;请您详细解答一下这些疑问,万分感谢。

Re: RDDRONE-BMS772 Development Board Accessories RDDRONE-BMS772开发板配件

Dear Fan007,

For battery state estimation research, the RDDRONE-BMS772 supports real 3S to 6S Li-ion/LiPo battery packs (6 V to 26 V) and does not require a specific battery model. The selected battery must include a cell-balancing connector. 
A charger compatible with the selected battery chemistry and cell count is required. No dedicated BMS communication interface is needed, as the RDDRONE-BMS772 can disconnect the charging path when necessary.
For firmware development and debugging, NXP recommends an external SWD debugger such as a PEMicro Universal Multilink or SEGGER J-Link Mini. The RDDRONE-BMS772 does not include an onboard USB debug interface, so an external debugger is necessary. These debuggers are commercially available.
For battery characterization and SOC/SOH algorithm development, a programmable electronic load (E-load) is also highly recommended to perform controlled charge/discharge testing. 
 
With Best Regards,
Jozef
タグ(1)
評価なし
バージョン履歴
最終更新日:
‎07-10-2026 02:29 AM
更新者: