Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Issue with Wi Fi CLI Open Thread CLI Dear Sir, We are using FRDM MCXW72 , to configure as OT-CLI  End node. We tried the procedure as per document UG10349. We are not able to go ahed after the step 5  i.e. Run the scripts to build all examples. $ ./script/build_mcxw72 after this command. Please guide resolve. FRDM-Training Re: Issue with Wi Fi CLI Open Thread CLI Hello, Hope you are doing well. MCXW72 does not support Wi-Fi, so no Wi-Fi CLI can work on this MCU. Could you please clarify what repository and release are you using? Best Regards, Ricardo Re: Issue with Wi Fi CLI Open Thread CLI Hi, Could you please clarify what repository and release are you using? The log indicates that the build is failing because the Arm GCC compiler cannot be found. The compiler path being used by CMake appears to be invalid, which suggests a toolchain path configuration issue. Could you please verify your ARMGCC_DIR configuration and confirm that arm-none-eabi-gcc is installed and accessible from that location? Once the compiler is correctly detected, the build should proceed further. Regards, Ricardo Re: Issue with Wi Fi CLI Open Thread CLI We are trying to use FRDM MCXW72 for OT CLI. Re: Issue with Wi Fi CLI Open Thread CLI Dear Sir, We are trying  code FRDMRW612 _Wifi_IPv4_IPv6_Echo on FRDM RW612 Its working TCP server we are able to get the echo as per attached. Now we are working to modify code for LED ON connected on port  GPIO 27 on FRDM Tried to do related changes in Config Pin as well as in the file socket_task.c We found the responce  is not coming on the terminal window after reset  but  Blue LED is glowing on FRDM board. Please communicate the resolution on the issue. We are not able to send the code as code size .zip is extending limit of 50Mb. Regards Seema Joshi Re: Issue with Wi Fi CLI Open Thread CLI Dear Sir, Arm GCC compiler   path is  C:\Program Files (x86)\GNU Arm Embedded Toolchain\10 2021.10 Please let us know how to set compiler path for CMAKE. Also please let us know about  how to verify ARMGCC_DIR configuration and confirm that arm-none-eabi-gcc is installed and accessible from that location? Regards Seema Joshi
View full article
SPI communication failed in DMA mode(S32k328) A hardware error will occur when serial port output is attempted after calling the Rm_Init(&Rm_Config); function. Comment out Rm_Init(&Rm_Config) and call  The status remains busy; I have only listed the key initialization functions. if (Lpspi5_ready_flag == 0u) { spi_status = Lpspi_Ip_AsyncTransmit(&LPSPI5_EXTERNAL_DEVICE, &Spi5TxBuffer[0], &Spi5RxBuffer[0], NUMBER_OF_BYTES, Spi5_EndCallback); if (spi_status != LPSPI_IP_STATUS_SUCCESS) { printf("SpiTp: AsyncTransmit FAIL\r\n"); return; } } static void system_init(void) { /* Initialize Clock */ Clock_Ip_StatusType Status_Init_Clock = CLOCK_IP_ERROR; Status_Init_Clock = Clock_Ip_Init(Clock_Ip_aClockConfig); /* Initialize all pins using the Port driver */ Siul2_Port_Ip_PortStatusType Status_Init_Port = SIUL2_PORT_ERROR; Status_Init_Port = Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS_PortContainer_0_BOARD_InitPeripherals, g_pin_mux_InitConfigArr_PortContainer_0_BOARD_InitPeripherals); /* Initialize interrupt */ IntCtrl_Ip_Init(&IntCtrlConfig_0); /* Initialize Dma */ IntCtrl_Ip_EnableIrq(DMATCD0_IRQn); IntCtrl_Ip_EnableIrq(DMATCD1_IRQn); Dma_Ip_Init(&Dma_Ip_xDmaInitPB); Dma_Mux_Ip_Init(&Dma_Mux_Config); //Rm_Init(&Rm_Config); } /* Initialize each Spi hardware units using*/ Lpspi_Ip_Init(&Lpspi_Ip_PhyUnitConfig_SpiPhyUnit_0_Instance_4); Lpspi_Ip_Init(&Lpspi_Ip_PhyUnitConfig_SpiPhyUnit_1_Instance_5); Lpspi_Ip_Init(&Lpspi_Ip_PhyUnitConfig_SpiPhyUnit_2_Instance_3); /* Update Framesize */ Lpspi_Ip_UpdateFrameSize(&LPSPI4_EXTERNAL_DEVICE, 8U); Lpspi_Ip_UpdateFrameSize(&LPSPI5_EXTERNAL_DEVICE, 8U); Lpspi_Ip_UpdateFrameSize(&LPSPI3_EXTERNAL_DEVICE, 8U); /* Update Transfered Bit order */ Lpspi_Ip_UpdateLsb(&LPSPI4_EXTERNAL_DEVICE, TRUE); Lpspi_Ip_UpdateLsb(&LPSPI5_EXTERNAL_DEVICE, TRUE); Lpspi_Ip_UpdateLsb(&LPSPI3_EXTERNAL_DEVICE, TRUE); /* Update Transfer Mode */ Lpspi_Ip_UpdateTransferMode(LPSPI4_EXTERNAL_DEVICE.Instance, LPSPI_IP_INTERRUPT); Lpspi_Ip_UpdateTransferMode(LPSPI5_EXTERNAL_DEVICE.Instance, LPSPI_IP_INTERRUPT); Lpspi_Ip_UpdateTransferMode(LPSPI3_EXTERNAL_DEVICE.Instance, LPSPI_IP_INTERRUPT); /* SPI5 AsyncTransmit 完成回调 */ static void Spi5_EndCallback(uint8 Instance, Lpspi_Ip_EventType Event) { (void)Instance; if (Event == LPSPI_IP_EVENT_END_TRANSFER) { Spi5TransferOk = TRUE; Spi5TransferFault = FALSE; } else /* LPSPI_IP_EVENT_FAULT */ { Spi5TransferFault = TRUE; Spi5TransferOk = FALSE; } Spi5TransferDone = TRUE; } Re: SPI communication failed in DMA mode(S32k328) Hi, @VaneB Based on your reply, I changed the RM configuration DMAMUX source to channel 16 and channel 17, and the DMA is also set to the corresponding channel 16 and channel 17. 1. I commented out Rm_Init(&Rm_Config); reserve Dma_Mux_Ip_Init(&Dma_Mux_Config); The interrupt was triggered normally. 2. I commented out Dma_Mux_Ip_Init(&Dma_Mux_Config); reserve Rm_Init(&Rm_Config); It will still trigger a hardware error. It's working properly now. It would be perfect if this problem could be solved. Thank you so much! BR, zyzzzz Re: SPI communication failed in DMA mode(S32k328) Hi @zyzzzz  I have an observation regarding your configuration. You have configured LPSPI5 to use DMA; however, in the RM configuration, the DMA MUX sources assigned to Channel 0 and Channel 1 correspond to LPSPI_1, not LPSPI_5.  Also, if you are already calling: Dma_Mux_Ip_Init(&Dma_Mux_Config); there is no need to also call: Rm_Init(&Rm_Config); Or vice versa. This is because Rm_Init() internally performs the following initialization sequence: Rm_Init() └─ Rm_InitGroup1() └─ Rm_Ipw_Dma_Mux_Init() └─ Dma_Mux_Ip_Init() As a result, the DMA MUX is being initialized twice. I would recommend keeping only one initialization function.  BR, VaneB Re: SPI communication failed in DMA mode(S32k328) Hi @zyzzzz  I noticed that you are configuring the DMA channels using DMAMUX0. However, if you refer to the S32K3xx_DMAMUX_map.xlsx file included with the Reference Manual, you can verify that the LPSPI_5 DMA request is mapped to DMAMUX1, not DMAMUX0. Please update the configuration to use DMAMUX instance 1 instead of instance 0. Re: SPI communication failed in DMA mode(S32k328) Hi, @VaneB I'm glad to receive your reply. I understand what you mean, but DMAMUX instance 1 cannot be selected at this time. If you select DMA_INSTANCE_0 and then select DMA Hardware Channel 16, you can select DMA Mux Source as DMA_MUX_1_LPSPI_5_TX_REQUEST.
View full article
S32 Design Studio for ARM v2.2 license extended Hello, I need help extending the activation period for my S32 Design Studio for ARM v2.2 installation. Activation Code: FAF2-FCC2-8A8E-87AC. Thank you! Hello, I need help extending the activation period for my S32 Design Studio for ARM v2.2 installation. Activation Code: FAF2-FCC2-8A8E-87AC. Thank you! Re: S32 Design Studio for ARM v2.2许可延期 Hello, We have extended your license. Best regards, Peter
View full article
MIMXRT1170およびMIMXRT1180における外部メモリインターフェースのECCサポートについての説明が必要です NXPチームの皆様、こんにちは。 メモリの整合性が重要な要件である重要なアプリケーションに対して、 MIMXRT1170 と MIMXRT1180 を評価しています。そのため、これらのデバイスにおける正確なECCカバレッジを理解することは、当社のアーキテクチャ設計およびデバイス選定プロセスにおいて非常に重要です。 利用可能なドキュメントを検討したものの、 どの外部メモリインターフェースがECC保護を提供し、そのECCがどのように実装されているかについて明確な概要を見つけることができませんでした。 1. 外部インターフェースECCカバレッジ MIMXRT1170とMIMXRT1180の両方で、以下のインターフェースのうちどれがECCをサポートしていますか? FlexSPI NORフラッシュ FlexSPI HyperFlash FlexSPI HyperRAM SEMC SDRAM SEMC SRAM/PSRAM EMMC SDカード・インターフェース その他の外部メモリインターフェース(該当する場合) 2. ECCの実装 対応する各インターフェースについて: ECCはハードウェアコントローラーからネイティブで提供されていますか? ECCはハードウェアで自動的にアクティブですか、それともソフトウェアの設定が必要ですか? 3. XECCの使用方法(RT1170) リファレンスマニュアルではXECCモジュールについて論じています。しかし、それが外部記憶とどのように関係しているかは完全には明確ではありません。 もう少し詳しく教えていただけますか: XECCで保護できるメモリやインターフェースはどれですか? XECCは内部メモリ専用ですか?それとも外部SDRAM、SRAM、HyperRAM、フラッシュなどに保存されたデータを保護することも可能でしょうか? 外部メモリインターフェースに対するXECC保護を示す使用例やアプリケーションノートはありますか? よろしくお願いいたします。 プージャ Re: Clarification Required on ECC Support for External Memory Interfaces in MIMXRT1170 and MIMXRT118 i.MX RT1170 ECCアプリケーションECCのイネーブルメントについては、AN13204を参照してください。 ECCは主に内部メモリ向けであり、外部メモリ向けとしては、主にNANDフラッシュメモリ(並列接続と直列接続の両方)向けである。詳細な情報はUMで確認できます。ECCにはどのような種類のメモリを使用したいですか? Re: Clarification Required on ECC Support for External Memory Interfaces in MIMXRT1170 and MIMXRT118 こんにちは、@Pooja_04 さん。 ご質問ありがとうございます! 1. 外部インターフェースECCカバレッジ MIMXRT1170 FlexSPIおよびSEMCコントローラ自体は外部メモリデータパスに対して汎用ネイティブECCを提供し ません。しかし、RT1170は それぞれFlexSPI1、FlexSPI2、SEMC に関連する3つの独立した外部ECCコントローラ(XECC)インスタンスを統合しています。eMMCおよびSDカード(uSDHC経由)にはMCU側のECC ありません。 MIMXRT1180 現在利用可能な製品ドキュメントでは、SEMC Raw NANDインターフェースのハードウェアECCが明示的に規定されています。SEMC SDRAM/SRAM、FlexSPI NOR/HyperFlash/HyperRAM、SD/eMMCの一般的なコントローラ側ECCは指定されておらず、RT1180のドキュメントにもRT1170スタイルのXECC_FLEXSPI/XECC_SEMCモジュールは されていません。 eMMC/SDデバイスは内部メディアECCを実装でき、SD/eMMCプロトコルは転送エラー検出にCRCを使用しますが、これらのメカニズムはMCU側のエンドツーエンドECC保護として扱うべきではありません。 2. ECCの実装 MIMXRT1170 — XECC(外部メモリ): ECCはFlexSPI/SEMCコントローラ ネイティブに提供されるわけではなく、専用のXECCモジュールによって提供されています。 ECCは自動的に有効化されません。ソフトウェア(または該当するROM/ヒューズフロー、ヒューズ経由)はECCアドレス領域を設定し、読み書きECCプロセッシングを有効化しなければなりません。 各XECCインスタンスは 4つの設定可能な保護アドレスウィンドウをサポートし、32ビットデータワードごとに32ビットのECCを拡張します。 領域全体は、読み取る前に初期化(プリロード)しておく必要があります。そうしないと、読み取り時にECCエラーが発生します。 MIMXRT1180 — SEMC NANDハードウェアECC: SEMコントローラハードウェアによってネイティブに提供され Raw NANDインターフェース(8/16ビット)用に  3. XECCの使用方法(RT1170) XECCは、 外部メモリ。 内部メモリ用ではありません — 内部TCM/キャッシュ/OCRAMは別々のECC機構(コア内蔵ECCとFlexRAM/MECCコントローラ)を使用します。 XECCは外部SDRAM、SRAM/PSRAM(SEMCの背後)、およびNOR Flash / HyperFlash / HyperRAM(FlexSPI1/FlexSPI2の背後)でデータを保護できます。 使用例/ドキュメント: AN13204 — 「i.MX RT1170 ECCアプリケーション」 (XECCの外部メモリ、ヒューズ/ソフトウェア設定、ROMプリロード、エラー注入をカバー): https://www.nxp.com/docs/en/application-note/AN13204.pdf (関連コード:AN13204SW) MCUXpresso SDK XECCの例 (RT1170/RT1160のみ) i.MX RT1170 リファレンスマニュアル(IMXRT1170RM) — XECC専用支部。 したがって、外部SDRAM/SRAMやFlexSPIフラッシュ/HyperRA MのECC保護が重要なアプリケーションに必須条件であれば、RT1170(XECC経由)    RT1180はそれを満たしますが、RT1180は同等の外部ECCコントローラを提供しません。RT1180ではコントローラ側の外部ECCはSEMC Raw NANDインターフェースに限定されます。 よろしくお願いします、 ギャビン
View full article
Wi-Fi CLI 问题(开放主题 CLI) 尊敬的先生, 我们使用 FRDM MCXW72 配置为 OT-CLI 终端节点。 我们按照文件 UG10349 中的方法进行了尝试。 第五步之后,我们无法继续进行下去。 IE运行脚本以版本所有示例。 $ ./script/build_mcxw72 执行此命令后。 请指导解决。 FRDM 培训 Re: Issue with Wi Fi CLI Open Thread CLI 你好, 希望你一切都好。MCXW72 不支持 Wi-Fi,因此任何 Wi-Fi CLI 都无法在该 MCU 上运行。 请问您使用的是哪个代码库和版本? 顺祝商祺! 里卡多 Re: Issue with Wi Fi CLI Open Thread CLI 我们正在尝试使用 FRDM MCXW72 进行 OT CLI。 Re: Issue with Wi Fi CLI Open Thread CLI 尊敬的先生, 我们正在 FRDM RW612 上尝试代码 FRDMRW612 _Wifi_IPv4_IPv6_Echo 这是正常工作的 TCP 服务器,我们能够获取到附件中的回显信息。 现在我们正在修改代码,以控制连接到 FRDM 芯片 GPIO 27 端口的 LED 灯亮起。 我尝试在 Config Pin 以及 socket_task.c 文件中进行相关更改。 我们发现 RESET 后终端窗口没有响应,但 FRDM 板上的蓝色 LED 灯亮着。 请告知问题的解决方案。 由于.zip文件大小超过了50Mb的限制,我们无法发送该代码。 此致 西玛·乔希 Re: Issue with Wi Fi CLI Open Thread CLI 您好, 请问您使用的是哪个代码库和版本? 日志显示构建失败,因为找不到 Arm GCC 编译器。CMake 使用的编译器路径似乎无效,这表明工具链路径配置存在问题。 请您检查一下您的 ARMGCC_DIR 配置,并确认 arm-none-eabi-gcc 是否已安装并可从该位置访问?一旦正确检测到编译器,版本就应该继续进行。 此致, 里卡多 Re: Issue with Wi Fi CLI Open Thread CLI 尊敬的先生, Arm GCC 编译器路径为 C:\Program Files (x86)\GNU Arm Embedded Toolchain\10 2021.10 请与我们联系如何为 CMAKE 设置编译器路径。 另外,请与我们联系 如何验证 ARMGCC_DIR 配置并确认 arm-none-eabi-gcc 已安装并可从该位置访问? 此致 西玛·乔希
View full article
i.MX8M Plus - SD2_VSEL fixed at 3.3V Hi Team, I have a requirement of SD2 Voltage at 3.3V. I dont want 1.8V in my design. So Can I place PD in SD_VSEL (PMIC Pin) so that Voltage is fixed at 3.3V? Also I can save one GPIO pin from SoC Is it okay to proceed with HW Control and no SW Control will be provided? i.MX 8 Family | i.MX 8QuadMax (8QM) | 8QuadPlus Re: i.MX8M Plus - SD2_VSEL fixed at 3.3V HI @ramkrish, Thank you for contacting NXP Support! On the EVK, the SD card voltage switching signal is connected to a GPIO of the processor. The SD driver automatically switches between 3.3V and 1.8V during the card initialization and negotiation process. If a high speed microSD card is detected and both the card and host support lower voltage operation, the driver will transition to 1.8V signaling to enable higher performance modes. You can also control the SD interface voltage manually if required. However, the system is already designed to handle the voltage transition automatically whenever the operating conditions require it. Best regards, Chavira
View full article
DMAモードでのSPI通信が失敗しました(S32k328) Rm_Init(&Rm_Config); 関数を呼び出した後、シリアルポート出力を試みるとハードウェアエラーが発生します。 Rm_Init(&Rm_Config) をコメントアウトして呼び出します。  ステータスは「ビジー」のままです。主要な初期化関数のみをリストアップしました。 if (Lpspi5_ready_flag == 0u) { spi_status = Lpspi_Ip_AsyncTransmit(&LPSPI5_EXTERNAL_DEVICE, &Spi5TxBuffer[0], &Spi5RxBuffer[0], NUMBER_OF_BYTES, Spi5_EndCallback); if (spi_status != LPSPI_IP_STATUS_SUCCESS) { printf("SpiTp: AsyncTransmit FAIL\r\n"); return; } } static void system_init(void) { /* Initialize Clock */ Clock_Ip_StatusType Status_Init_Clock = CLOCK_IP_ERROR; Status_Init_Clock = Clock_Ip_Init(Clock_Ip_aClockConfig); /* Initialize all pins using the Port driver */ Siul2_Port_Ip_PortStatusType Status_Init_Port = SIUL2_PORT_ERROR; Status_Init_Port = Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS_PortContainer_0_BOARD_InitPeripherals, g_pin_mux_InitConfigArr_PortContainer_0_BOARD_InitPeripherals); /* Initialize interrupt */ IntCtrl_Ip_Init(&IntCtrlConfig_0); /* Initialize Dma */ IntCtrl_Ip_EnableIrq(DMATCD0_IRQn); IntCtrl_Ip_EnableIrq(DMATCD1_IRQn); Dma_Ip_Init(&Dma_Ip_xDmaInitPB); Dma_Mux_Ip_Init(&Dma_Mux_Config); //Rm_Init(&Rm_Config); } /* Initialize each Spi hardware units using*/ Lpspi_Ip_Init(&Lpspi_Ip_PhyUnitConfig_SpiPhyUnit_0_Instance_4); Lpspi_Ip_Init(&Lpspi_Ip_PhyUnitConfig_SpiPhyUnit_1_Instance_5); Lpspi_Ip_Init(&Lpspi_Ip_PhyUnitConfig_SpiPhyUnit_2_Instance_3); /* Update Framesize */ Lpspi_Ip_UpdateFrameSize(&LPSPI4_EXTERNAL_DEVICE, 8U); Lpspi_Ip_UpdateFrameSize(&LPSPI5_EXTERNAL_DEVICE, 8U); Lpspi_Ip_UpdateFrameSize(&LPSPI3_EXTERNAL_DEVICE, 8U); /* Update Transfered Bit order */ Lpspi_Ip_UpdateLsb(&LPSPI4_EXTERNAL_DEVICE, TRUE); Lpspi_Ip_UpdateLsb(&LPSPI5_EXTERNAL_DEVICE, TRUE); Lpspi_Ip_UpdateLsb(&LPSPI3_EXTERNAL_DEVICE, TRUE); /* Update Transfer Mode */ Lpspi_Ip_UpdateTransferMode(LPSPI4_EXTERNAL_DEVICE.Instance, LPSPI_IP_INTERRUPT); Lpspi_Ip_UpdateTransferMode(LPSPI5_EXTERNAL_DEVICE.Instance, LPSPI_IP_INTERRUPT); Lpspi_Ip_UpdateTransferMode(LPSPI3_EXTERNAL_DEVICE.Instance, LPSPI_IP_INTERRUPT); /* SPI5 AsyncTransmit 完成回调 */ static void Spi5_EndCallback(uint8 Instance, Lpspi_Ip_EventType Event) { (void)Instance; if (Event == LPSPI_IP_EVENT_END_TRANSFER) { Spi5TransferOk = TRUE; Spi5TransferFault = FALSE; } else /* LPSPI_IP_EVENT_FAULT */ { Spi5TransferFault = TRUE; Spi5TransferOk = FALSE; } Spi5TransferDone = TRUE; } Re: SPI communication failed in DMA mode(S32k328) こんにちは、 @VaneB ご回答に基づき、 RM構成のDMAMUXソースをチャンネル16とチャンネル17に変更し、DMAも対応するチャンネル16とチャンネル17に設定しました。 1. コメントアウトしました Rm_Init(&Rm_Config); 予約する Dma_Mux_Ip_Init(&Dma_Mux_Config); 割り込みは正常に発生しました。 2. コメントアウトしました Dma_Mux_Ip_Init(&Dma_Mux_Config); 予約する Rm_Init(&Rm_Config); それでもハードウェアエラーが発生します。 今は正常に動作しています。この問題が解決すれば完璧です。本当にありがとうございました! BR、zyzzzz Re: SPI communication failed in DMA mode(S32k328) こんにちは@zyzzzz あなたの設定に関して、一つ気づいた点があります。LPSPI5をDMAを使用するように設定していますが、しかし、RM構成では、チャネル0とチャネル1に割り当てられたDMAのMUXソースはLPSPI_1に対応し、LPSPI_5に対応していません。 また、既に電話をかけている場合は、 Dma_Mux_Ip_Init(&Dma_Mux_Config); また、以下の番号に電話する必要はありません。 Rm_Init(&Rm_Config); あるいはその逆も然り。これは、Rm_Init() が内部的に以下の初期化シーケンスを実行するためです。 Rm_Init() └─ Rm_InitGroup1() └─ Rm_Ipw_Dma_Mux_Init() └─ Dma_Mux_Ip_Init() その結果、DMAマルチプレクサが2回初期化されることになる。初期化関数は1つだけにしておくことをお勧めします。 BR、VaneB Re: SPI communication failed in DMA mode(S32k328) こんにちは@zyzzzz DMAチャネルの設定はDMAMUX0を使っているのに気づきました。ただし、リファレンスマニュアルに付属するS32K3xx_DMAMUX_map.xlsxファイルを参照すれば、LPSPI_5 DMA要求がDMAMUX0ではなくDMAMUX1にマッピングされていることを確認できます。 DMAMUXインスタンス0ではなくインスタンス1を使用するように設定を更新してください。 Re: SPI communication failed in DMA mode(S32k328) こんにちは、 @VaneB ご返信ありがとうございます。おっしゃることは理解できますが、現時点ではDMAMUXインスタンス1を選択することはできません。 DMA_INSTANCE_0を選択してからDMAハードウェアチャネル16を選択すると、DMA MuxソースとしてDMA_MUX_1_LPSPI_5_TX_REQUESTを選択できます。
View full article
#S32K312 IO 输入配置 joshua9264_0-1783597102225.png 我想使用LPUART0 RX,需要配置IMCR[699],但规范中只列出了IMCR[473],那我该怎么办? Re: #S32K312 IO input config 嗨@joshua9264 S32K3xx 参考手册第 12 版第 10.1.2 节指出: “附件 IOMUX 文件中定义的 IMCR 相对于 SIUL2 内存映射部分中定义的 IMCR 编号有 512 的偏移量。” 为了帮助阐明如何应用偏移量,RM 第 4.4.3 节还提供了一个示例。 BR,VaneB Re: #S32K312 IO input config 是的,我找到了。谢谢
View full article
关于MIMXRT1170和MIMXRT1180中外部存储器接口的ECC支持需要进一步说明 您好,NXP团队, 我们正在评估MIMXRT1170和MIMXRT1180在内存完整性是关键要求的关键应用中的性能。因此,了解这些设备上的确切 ECC 覆盖范围对于我们的架构和设备选择过程非常重要。 在查阅了现有文档后,我们未能找到关于哪些外部存储器接口提供 ECC 保护以及如何实现 ECC 的清晰总结。 1. 外部接口 ECC 覆盖范围 对于 MIMXRT1170 和 MIMXRT1180,下列哪些接口支持 ECC? FlexSPI NOR闪存 FlexSPI HyperFlash FlexSPI 超级内存 SEMC 同步动态随机存取存储器(SDRAM) SEMC SRAM/PSRAM eMMC SD卡接口 其他外部存储器接口(如有) 2. ECC实施 对于每个支持的接口: 硬件控制器是否原生支持ECC? ECC功能在硬件中是自动激活的,还是需要软件配置? 3. XECC 的使用 (RT1170) 参考手册讨论了 XECC 模块;但是,它与外部存储器的关系并不完全清楚。 请问您能否解释一下: 哪些存储器/接口可以通过 XECC 进行保护? XECC 是否仅适用于内部存储器,还是也可以保护存储在外部 同步动态随机存取存储器(SDRAM)、SRAM、HyperRAM、闪存等中的数据? 是否有任何使用示例或应用笔记来展示 XECC 对外部存储器接口的保护? 问候, Pooja Re: Clarification Required on ECC Support for External Memory Interfaces in MIMXRT1170 and MIMXRT118 i.MX RT1170 ECC 应用您可以参考 AN13204 了解 ECC 启用方法。 ECC主要用于内部存储器,对于外部存储器,ECC主要用于并行和串行的与非设备。您可以访问UM网站查看详细信息。你想使用哪种类型的内存进行ECC纠错? Re: Clarification Required on ECC Support for External Memory Interfaces in MIMXRT1170 and MIMXRT118 你好@Pooja_04 , 谢谢你的提问! 1. 外部接口 ECC 覆盖范围 MIMXRT1170 FlexSPI 和 SEMC 控制器 本身并不为外部存储器数据路径提供通用的原生 ECC。然而,RT1170集成了 三个独立的外部ECC控制器(XECC)实例,分别与 FlexSPI1、FlexSPI2 和 SEMC。eMMC 和 SD 卡(通过 uSDHC) 没有MCU端ECC。 MIMXRT1180 目前的产品文档明确规定了 SEMC Raw NAND 接口的硬件 ECC。确实如此。 RT1180 文档并未指定 SEMC SDRAM/SRAM、FlexSPI NOR/HyperFlash/HyperRAM 或 SD/eMMC 的通用控制器端 ECC。 无法识别 RT1170 型 XECC_FLEXSPI / XECC_SEMC 模块。eMMC/SD 设备可能实现内部介质 ECC,SD/eMMC 协议使用 CRC 进行传输错误检测,但这些机制不应被视为 MCU 端到端 ECC 保护。 2. ECC实施 MIMXRT1170 — XECC(外部存储器): ECC是 FlexSPI/SEMC 控制器本身不提供此功能;此功能由专用的 XECC 模块提供。 ECC不会自动启用。软件(或适用的 ROM/熔丝流程,通过熔丝)必须配置 ECC 地址区域并启用读/写 ECC 处理。 每个 XECC 实例支持 它具有四个可配置的受保护地址窗口,并且每个 32 位数据字都带有 32 位 ECC。 必须先初始化(预加载)整个区域,然后才能读取;否则读取操作将引发 ECC 错误。 MIMXRT1180 — SEMC 与非硬件 ECC: Provided natively by the SEMC controller hardware for the RAW NAND interface (8/16-bit). 3. XECC 的使用 (RT1170) XECC 旨在用于 外部存储器。这是 不适用于内部存储器——内部 TCM/Cache/OCRAM 使用独立的 ECC 机制(内核内置 ECC 和 FlexRAM/MECC 控制器)。 XECC 可以保护外部 同步动态随机存取存储器(SDRAM)、SRAM/PSRAM(SEMC 后面)和 NOR Flash / HyperFlash / HyperRAM(FlexSPI1/FlexSPI2 后面)中的数据。 使用示例/文档: AN13204 — “i.MX RT1170 ECC 应用” (涵盖外部存储器的 XECC、熔丝/软件配置、ROM 预加载、错误注入): https://www.nxp.com/docs/en/application-note/AN13204.pdf (配套代码:AN13204SW) MCUXpresso SDK XECC 示例 (仅限RT1170/RT1160) i.MX RT1170 参考手册 (IMXRT1170RM) — 专用的 XECC 分会。 因此,如果ECC保护 外部 SDRAM/SRAM 或 FlexSPI Flash/HyperRAM 这是您的关键应用程序的硬性要求。 RT1170(通过 XECC) 符合这一点,而 RT1180 没有提供等效的外部 ECC 控制器——在 RT1180 上,控制器侧的外部 ECC 仅限于 SEMC RAW NAND 接口。 此致, 加文
View full article
利用管道进行日志记录 大家好, 我正在尝试集成 freemaster pipes 进行日志记录(以后可能会用到它的更多功能)。 由于我使用的是 Linux 系统,所以我尝试了 freemaster light + python 的方案。 我可以正常连接,但是当尝试打开管道并打印管道日志消息时,我没有通过 rpc 服务器收到任何数据。 为了验证目标实现,我还通过 Windows GUI 进行了检查,发现它可以正确读取管道,因此问题似乎出在 PC 端。 请参见附件中的示例 Python 脚本。任何提示都欢迎。 顺祝商祺! Re: Utilize pipe for logging 没关系,看来我需要在接收端显式调用 PipeFlush 函数。没想到会这样。附件为可运行示例,供您参考。 Re: Utilize pipe for logging 你好, 太好了,你终于搞定了。我确认需要调用 PipeFlush 函数,因为它会导致管道数据在两个方向上交换。实际上,这是唯一一个会导致物理数据传输的管道调用。PC 端和目标端的所有其他操作都只是将数据缓冲到管道缓冲区。 使用 FreeMASTER 协议时,PC 是唯一的通信启动器。目标板无法自行启动。PipeFlush 是 PC 给目标用户一个机会来报告(然后发送)任何新的管道数据的地方。 问候, 米哈尔
View full article
LS1088AのDDRvツールに問題があります こんにちは、LS1088A SoCベースのカスタムボード上で新しいタイプのDDR4 SO-DIMMを検証しようとしているのですが、DDRvで問題が発生しています。過去にいくつかのDDR4モデルを検証しましたが、問題は発生しませんでした。 私が検証しようとしている新しいDDRモデルは、メンフィスのB075I IMM2G72D4SOD8AGです。その速度制限は2,666ですが、2,100MT/sで運行したいと考えています。QorQの新しい構成プロジェクトを作成し、SPD経由でDDR構成を正常に読み込むことができました。しかし、最初のステップ(クロックのセンタリング)は「自動検索と書き込みレベリング開始値の検出」部分で0.04%で一貫して失敗します。 テスト結果の概要を見ると、テストが失敗し、理由は「DDRインターフェースがWRLVL_START値以外の原因で故障しています。ボードのハードウェア問題を調査してください。" ログセクションには、以下の情報が表示されます。 ################## ## Result for: wrlvl_searcher ## ## ## Run  1 ## ####################################   テスト結果: [ ============================================================ 更新: WRLVL_CNTL = 0x86550605、WRLVL_CNTL_2 = 0x00000000、WRLVL_CNTL_3 = 0x00000000、SDRAM_CLK_CNTL = 0x02800000     ============================================================ 更新: WRLVL_CNTL = 0x86550607、WRLVL_CNTL_2 = 0x09060C0F、WRLVL_CNTL_3 = 0x0E110B0E、SDRAM_CLK_CNTL = 0x02800000     ============================================================ 更新: WRLVL_CNTL = 0x86550607、WRLVL_CNTL_2 = 0x09050C0F、WRLVL_CNTL_3 = 0x1611130E、SDRAM_CLK_CNTL = 0x02800000     DDRインターフェースがWRLVL_START値以外の原因で故障しているので、基板のハードウェア問題を調査してください。 <> {{DDR interface is failing due to an issue other than WRLVL_START values, please investigate HW issues on the board.}}     エラーキャプチャレジスタ: 0xE20、0x00000000 0xE24、0x00000000 0xE28、0x00000000 0xE40、0x00000080 0xE44、0x00000000 0xE48、0x0000001D 0xE4C、0x00000000 0xE50、0x00000000 0xE54、0x00000000 0xE58、0x00010000     ごみ: 0xF00、0x00000000 0xF04、0x00001002 0xF08、0x0000000A 0xF0C、0x14000C20 0xF10、0x00000000 0xF14、0x00000000 0xF18、0x00000000 0xF1C、0x00000000 0xF20、0x00000000 0xF24、0x2F003500 0xF28、0x2A003600 0xF2C、0x3E004A00 0xF30、0x44004600 0xF34、0x3A007000 0xF38、0x00000000 0xF3C、0x00000000 0xF40、0x00000000 0xF44、0x00000000 0xF48、0x00000001 0xF4C、0x94000000 0xF50、0x0F001300 0xF54、0x0C001800 0xF58、0x1F002C00 0xF5C、0x22002700 0xF60、0x1C000000 0xF64、0x00009000 0xF68、0x00000020 0xF6C、0x00000000 0xF70、0x0060007B 0xF74、0x00000000 0xF78、0x00000000 0xF7C、0x00000000 0xF80、0x00000000 0xF84、0x00000000 0xF88、0x00000000 0xF8C、0x00000000 0xF90、0x00000000 0xF94、0x80000000 0xF98、0x00000000 0xF9C、0x29002B00 0xFA0、0x2B002B00 0xFA4、0x27002D00 0xFA8、0x28002E00 0xFAC、0x27000000 0xFB0、0x10000003 0xFB4、0x42344241 0xFB8、0x40334332 0xFBC、0x43404150 0xFC0、0x00004133 0xFC4、0x44424444 0xFC8、0x44415134 0xFCC、0x51414251 0xFD0、0x42414241 0xFD4、0x50434252 0xFD8、0x50444342 0xFDC、0x42413444 0xFE0、0x43514340 0xFE4、0x44424444 0xFE8、0x42514441 0xFEC、0x40423443 0xFF0、0x43424342 0xFF4、0x43415042 0xFF8、0x51415341 0xFFC、0x54000D0D       データ: 0x00000005 0x00000000 0x00000000 0x00000000 0x00000000 0x00000000 0x00000000 0x00000000 0x00000000   ]   検証手順が失敗した際の詳細なCCSログも添付しました。   これが何を意味するのか、また問題のデバッグ方法を説明していただけますか? QorIQ LS1デバイス Re: Problem with DDRv tool on LS1088A 新しいタイプのDDR4 SO-DIMMと比べて、以前使われていたSODIMMはどのようなものでしたか?新旧間の変更点 Re: Problem with DDRv tool on LS1088A こんにちは、 あなたの具体的なダンプに関して最も有効な解釈は、コントローラがトレーニング中に自動キャリブレーションエラー( ACE )を発生させ、DDRvの書き込みレベリング検索が調整しても有効な動作領域を見つけられなかった WRLVL_START です。これはまずリセット/クロック/構成/DQマップ/SIチェックを指し示しており、DDRリセットと DQn_MAP は、NXPのデバッグ履歴においてこのDDRv障害クラスに繰り返し関連付けられているため、優先順位が高い。ですので、チューニングマージンを決める前にDDRクロック/RCW、DDRリセットタイミング、SPD由来のランク/ジオメトリ、DQマッピング、パワー/SIを確認してください。 よろしくお願いします。
View full article
S32K3のeTPUクランク、カム、インジェクション、イグニッション こんにちは、 クランクとカムの信号に合わせてインジェクションと点火を作動させるドライバを実装する必要があります。 このドライバを実装するための最適なソリューションを理解する必要があります。 私の疑問は次のとおりです: 1) AN4907SW.zip で提供される API は、S32K3xx に存在する eTPU と互換性がありますか? 2)いいえの場合、この API を S32K3xx に適合させるのは良い解決策ですか、それとも ConfigTool を使用するのが最善の解決策でしょうか? このアプリケーションについて S32K3xx の例はありますか? よろしく、フランチェスコ。 Re: eTPU crank, cam, injections and Ignitions on S32K3 こんにちは@francescovico ビッグ エンディアンからリトルエンディアンにデータを変換するには、データ型のサイズに応じてビット シフトとマスクを調整してバイト順序を逆にする必要があります。 GCC は、このプロセスを簡素化する組み込み関数を提供します。例: uint32_t __builtin_bswap32 (uint32_t x)。詳細については、GCC ドキュメントの7.2.3 バイトスワッピング組み込みを参照してください。 Re: eTPU crank, cam, injections and Ignitions on S32K3 こんにちは@VaneB 、 私が正しく理解していれば、オートモーティブ機能 (CRANK、SPARK...) はビッグエンディアンマイクロコントローラ用に作られています。 S32K364 (リトルエンディアン) 上のオートモーティブ機能で eTPU を使用するには、次を選択して関数セットをダウンロードする必要があります。 francescovico_0-1761136257258.png そして関数を変更します: uint32_t *fs_memcpy32(uint32_t *dest、uint32_t *source、uint32_t size); void fs_memset32(uint32_t *開始、uint32_t 値、int32_t サイズ); 各 32 ビット値を交換して、リトルエンディアン コードとパラメータを読み書きするというのは本当ですか? よろしく、フランチェスコ。 Re: eTPU crank, cam, injections and Ignitions on S32K3 こんにちは@francescovico 電動化アプリケーション向け S32K39/37/36 マイクロコントローラにはeTPU が含まれています。ただし、現在、これらのデバイス向けに利用できる MPC5634 の AN4907 に類似した専用のドキュメントやデモはありません。 ただし、AN4907 ドキュメント、デモ、マイクロコードは S32K39/37/36 ファミリに適していますが、これらのデバイスはリトルエンディアン アーキテクチャを使用していることに注意してください。したがって、メモリ アクセス API を変更する必要があります。 リトルエンディアン に更新された CodeWarrior eTPU 関数セレクタ でモータ制御関連のモジュールを参照できます。 BR、ヴェインB Re: eTPU crank, cam, injections and Ignitions on S32K3 指摘していただきありがとうございます! エンディアン変換の問題が発生しました。その結果、欠落した歯のマスクが正しく構成されず、1 回転あたり 350 度、または 1 サイクルあたり 700 度とカウントされました。 現在、元の投稿のデモ アプリは修正されています。 Re: eTPU crank, cam, injections and Ignitions on S32K3 こんにちは@MilanBrejlさん、 現在、Fuel Cyl 1 etpu ドライバを使用しようとしています。 ドライバは s24AngleNormalEnd を「開始角度」として使用し、s24AngleStop で噴射を停止するようです。 u24InjectionTime の持続時間は決して尊重されません。 それは可能ですか? .rarが添付されていますインジェクターパラメータが以下の「燃料シリンダー 1」のピコスコープ取得を含むファイル: Etpu_Fuel_Ip_ConfigType fuel_1_config = { .s24角度法線終了= DEG2TCR2(-180)、 .s24アングルストップ= DEG2TCR2(-360)、 .s24角度オフセット再計算= DEG2TCR2(-30)、 .u24注入時間= USEC2TCR1(1200)、 .u24補償時間= USEC2TCR1(0)、 .u24注入時間最小値= USEC2TCR1(0)、 .u24オフタイム最小値= USEC2TCR1(0)、 .eGenerationDisable= ETPU_FUEL_GENERATION_ALLOWED }; ピコスコープ取得では、正確に 180° で注入が開始され、360° で注入が停止し、注入持続時間が 30 ms (1.2 ms であるべき) であることが確認できます。 よろしく、フランチェスコ。 Re: eTPU crank, cam, injections and Ignitions on S32K3 こんにちは@MilanBrejlさん、 現在、Fuel Cyl 1 etpu ドライバを使用しようとしています。 ドライバはs24AngleNormalEnd を「開始角度」として使用し、s24AngleStop ですべての噴射を停止するようです。 u24InjectionTime の持続時間は決して尊重されません。 それは可能ですか? .rarが添付されていますインジェクターパラメータが以下の「燃料シリンダー 1」のピコスコープ取得を含むファイル: Etpu_Fuel_Ip_ConfigType fuel_1_config = { .s24角度法線終了= DEG2TCR2(-180)、 .s24アングルストップ= DEG2TCR2(-360)、 .s24角度オフセット再計算= DEG2TCR2(-30)、 .u24注入時間= USEC2TCR1(1200)、 .u24補償時間= USEC2TCR1(0)、 .u24注入時間最小値= USEC2TCR1(0)、 .u24オフタイム最小値= USEC2TCR1(0)、 .eGenerationDisable= ETPU_FUEL_GENERATION_ALLOWED }; ピコスコープ取得では、正確に 180° で注入が開始され、360° で注入が停止し、注入持続時間が 30 ms (1.2 ms であるべき) であることが確認できます。 よろしく、フランチェスコ。 Re: eTPU crank, cam, injections and Ignitions on S32K3 こんにちは@MilanBrejlさん、 おっしゃる通り、 s24AngleOffsetRecalc は正の数である必要がありますが、次のように記述します。 s24角度オフセット再計算 = DEG2TCR2(30) 結果は同じです(。 私は 16 チャネルの 2 つの ETPU (A と B) を備えた S32K364 を使用しています。 ETPUA で燃料ドライバーを使用するとドライバーは正常に動作しますが、ETPUB チャネル 0 を使用する必要があります。 私の必要性は、STAC レジスタを使用して、ETPUA から ETPUB に TCR1 と TCR2 を共有することです。 STAC レジスタが正しく初期化されていない可能性があります。 よろしく、フランチェスコ。 Re: eTPU crank, cam, injections and Ignitions on S32K3 こんにちは@francescovicoさん、 これは、eTPU1 から eTPU2 に TCR1 と TCR2 を共有するように STAC_ENG1 および STAC_ENG2 レジスタを設定する方法です。 MilanBrejl_0-1770199430269.png 役に立つかどうか教えてください。 よろしくお願いいたします。 ミラノ Re: eTPU crank, cam, injections and Ignitions on S32K3 こんにちは@MilanBrejlさん、 私のレジスターはあなたの提案と全く同じです: ETPU_A_B_REGISTER.png しかし、問題はまだ存在しています。 添付のピコスコープ取得では、ETPU A で生成されたスパークが青色で、ETPU B で生成されたスパークが赤色で確認できます。 両方のスパークの終了角度は 180 度、滞在時間は 8000 マイクロ秒です。 よろしく、フランチェスコ。   Re: eTPU crank, cam, injections and Ignitions on S32K3 こんにちは@francescovicoさん、 私のサイトでもあなたの問題を再現し、根本的な原因を見つけました。両方の eTPU エンジン間で TCR1/TCR2 時間/角度バスを共有するだけでは不十分です。スパークおよび燃料機能は、実際のエンジン速度に基づいて時間を角度に変換します。TRR(ティック レート レジスタ)を使用します。このレジスタは、Angle Clock ロジックの一部であり、eTPU A で実行される Crank eTPU 機能によって管理されます。したがって、TRR の正しい値は eTPU A でのみ保持されます。次に、eTPU B TRR を使用した eTPU B の時間から角度への変換で間違った結果が返されます。 これはかなり基本的な問題で、おそらく両方の eTPU エンジンでエンジン制御を実行している人に会ったことがないので、これは解決されていません。特に、新しい S32K3 デバイスは 16+16 チャネルに制限されているため、これは重要になります。このユースケースを提起していただき、またお待ちいただきありがとうございます。 添付のデモ アプリケーションは、(このスレッド内の) 以前のものに基づいており、次の変更が追加されています。 Spark 2 チャネルは eTPU エンジン A から eTPU エンジン B に移動されます。 MilanBrejl_0-1770672522362.png チャネルマスクはそれに応じて更新されます MilanBrejl_1-1770672675064.png チャネルリンクは両方のエンジンの使用をサポートする必要があります(マクロ ETPU_IP_CHANNEL_TO_LINK を使用) MilanBrejl_2-1770672729220.png ピン構成が更新され、割り込み構成が更新されました Crank eTPU FW の新機能: eTPU FW イメージが更新されました。Crank 関数は両方のエンジンで実行でき、他の eTPU エンジンの TRR 値も更新できます。 この新機能では、クランク構成に1つの新しいパラメータを設定する必要があります。 MilanBrejl_4-1770673143063.png どこ MilanBrejl_3-1770673103441.png これが役に立つことを願います。 よろしくお願いいたします。 ミラノ Re: eTPU crank, cam, injections and Ignitions on S32K3 こんにちは@MilanBrejlさん、 今では完璧に動作しています。 サポートしていただき本当にありがとうございます! よろしく、フランチェスコ。 Re: eTPU crank, cam, injections and Ignitions on S32K3 こんにちは。私もK396基板について調べており、クランクシャフト、カムシャフト、オイルインジェクターにETPUを使用したいと考えています。この件についてもう少し詳しくお話しいただけますでしょうか?
View full article
Utilize pipe for logging Hi community, I am trying to integrate freemaster pipes for logging (and maybe use more of its functionality later on). As I am running linux I tried to go the freemaster light + python path. I can properly connect but when trying to open the pipeline and print my piped log messages I am not receiving any data via the rpc server. To verify the target implementation I also checked via the Windows GUI which could read the pipe properly, so the issue seems to be on the PC side. See attached example python script. Any hints welcome. best regards Re: Utilize pipe for logging Never mind, seems I have to explicitly call PipeFlush on the receiver side. Did not expect that. Attached the working example as reference. Re: Utilize pipe for logging Hello,  it is great you got it finally working. I confirm the PipeFlush needs to be called as it causes the pipe data to be exchanged in both directions. This is actually the only pipe call which causes a physical data transfer. All other operations at both PC and target sides are just buffering the data to pipe buffers. When using FreeMASTER protocol, the PC is the only initiator of communication. The target board cannot start it by itself. The PipeFlush is the place where PC gives the target a chance to report (and then send) any new pipe data. Regards, Michal
View full article
マイクロコントローラ の選び方は?位置制御のためにエンコーダー付きのモーターを3つ制御する必要があります。 ステッピングやBLDCモーター(+モータ・ドライバまたはESC)で、xyz軸方向の負荷(例えば約3kg)の位置を制御したいと考えています。フィードバックループ用のエンコーダーやセンサも追加したいと思っています。 そのため、適切なマイクロコントローラを選ぶのに苦労しました。ブランドについては、STM32かESP32のどちらかにしようと考えています。3つのモーターがあるため、3つのPWM出力信号が必要ですが、クロック周波数や外部部品の必要性など、その他の要件が満たされているかどうかをどのように判断すればよいでしょうか? Re: How to choose a microcontroller? Need to control 3 motors with encoders for position control. こんにちは、 @pekomsさん MCXを選択する場合は、このプロジェクトではMCX A34x / A344~A346から始めてください。180 MHzのCortex-M33、2つのFlexPWM/eFlexPWMブロック、多数のPWM出力、ADC、タイマー、そしてエンコーダフィードバック用のハードウェア直交デコーダブロック2つを備えているため、3軸モーター制御に最も強力なMCX適合です。 カタログを精査した結果、この種のタスクに適したハイエンドMCXの主要候補として、MCX N94xとMCX A34xが浮上した。 BR ハリー
View full article
How to choose a microcontroller? Need to control 3 motors with encoders for position control. Im looking to control the position of a load (lets say around 3 kg) in xyz axis with either steppers or BLDC motors (+Drivers or ESC). I want to add encoders as well or some sensors for feedback loop. Based on that, I struggled to pick an appropriate microcontroller. I was thinking either STM32 or ESP32 for the brand. It requires 3 PWM output signals (since 3 motors), but how do I know if everything else is enough like the frequency of the clock, do I need external components, etc? Re: How to choose a microcontroller? Need to control 3 motors with encoders for position control. Hi @pekoms  For an MCX choice, start with MCX A34x / A344–A346 for this project. It is the strongest MCX fit for 3-axis motor control because it has a 180 MHz Cortex‑M33, two FlexPWM/eFlexPWM blocks, many PWM outputs, ADCs, timers, and two hardware quadrature decoder blocks for encoder feedback. A catalog pass also surfaced MCX N94x and MCX A34x as the main higher-end MCX candidates for this class of task. BR Harry
View full article
ログ記録にパイプを利用する こんにちは、コミュニティの皆さん、 ログ記録のためにfreemasterパイプを統合しようとしています(そして、将来的にはその他の機能も利用したいと思っています)。 Linuxを使っているので、FreeMaster Light + Pythonの道を試しました。 正常に接続はできますが、パイプラインを開いてパイプログメッセージを印刷しようとすると、rpcサーバー経由でデータが一切届きません。 ターゲット実装を確認するために、Windows GUIでパイプを正しく読み取れるか確認したので、問題はPC側にあるようです。 添付のPythonスクリプトの例を参照してください。どんなヒントでも歓迎です。 よろしくお願いいたします Re: Utilize pipe for logging まあいいや、レシーバでPipeFlushを明示的に呼ぶ必要があるようだ。それは予想外だった。参考として、動作例を添付しました。 Re: Utilize pipe for logging こんにちは、 ようやく動作するようになってよかったですね。PipeFlushを呼び出す必要があることを確認しました。なぜなら、この関数はパイプデータの双方向交換を引き起こすからです。これは、物理的なデータ転送を引き起こす唯一のパイプ呼び出しです。PC側とターゲット側の両方におけるその他の操作はすべて、データをパイプバッファにバッファリングするだけです。 FreeMASTERプロトコルを使用する場合、通信の開始者はPCのみとなります。ターゲットボードは自動で起動できません。PipeFlushは、PCがターゲットに対して新しいパイプデータを報告(そして送信)する機会を与える場所です。 よろしくお願いいたします。 ミハル
View full article
如何选择微控制器?需要使用编码器控制3个电机进行位置控制。 我希望使用步进电机或无刷直流电机(+驱动器或电调)来控制负载(假设约为 3 公斤)在 xyz 轴上的位置。我还想添加编码器或一些传感器用于反馈回路。 基于此,我很难选择合适的微控制器。我当时考虑的是STM32或者ESP32作为品牌。它需要 3 个 PWM 输出信号(因为有 3 个电机),但我如何知道其他方面是否足够,例如时钟频率、是否需要外部元器件等等? Re: How to choose a microcontroller? Need to control 3 motors with encoders for position control. 嗨@pekoms 对于 MCX 选择,本项目建议首先选择 MCX A34x / A344–A346。它是最适合三轴电机控制的 MCX,因为它具有 180 MHz Cortex-M33、两个 FlexPWM/eFlexPWM 模块、多个 PWM 输出、ADC、定时器和两个用于编码器反馈的硬件正交解码器模块。 目录浏览还发现 MCX N94x 和 MCX A34x 是此类任务的主要高端 MCX 候选产品。 BR 哈里
View full article
Gui_Guider may freeze when generating C code. After importing the font file, the generated C code keeps getting stuck. Even after I reduced the page to a single size and removed the icons to create a simple interface, it still gets stuck in the "Generating C code" state. Re: Gui_Guider在生成C code时会出现卡死的情况 I found the problem is that when I directly import a new font into Gui_Guider, the Generating C code freezes. How can I solve this problem? 回复: Gui_Guider在生成C code时会出现卡死的情况 Hi @vettle  May I ask what font you imported? Will this problem occur if you change the font? BR Harry
View full article
Gui_Guider在生成C code时会出现卡死的情况 在导入字体文件后生成C代码会出现一直生成的情况,我将页面缩减成一个,去除图标生成一个简单的界面也会一直卡在Generating C code的情况。 Re: Gui_Guider在生成C code时会出现卡死的情况 我发现原因就是我直接在Gui_Guider里导入一个新的字体然后Generating C code就会出现卡死,我如何解决这个问题? 回复: Gui_Guider在生成C code时会出现卡死的情况 嗨@vettle 请问您导入的是什么字体? 如果更改字体,还会出现这个问题吗? BR 哈里
View full article
Toolbox workflow 1 Table of Contents • Introduction • Overview • Context • References • Conclusion 2 Introduction This article provides a high-level overview of the typical workflow for developing an application using the toolbox. It explains how the main development stages fit together, from preparing the environment and selecting the target hardware to configuring the project, generating code, building the application, programming the target, and validating the results. The purpose of this topic is to help users understand the overall process and to guide them toward the related articles that describe each stage in more detail. 3 Overview Workflow Scope The workflow described in this article covers the main steps typically followed when developing an application with the toolbox. After the toolbox and supporting environment are prepared, the user can create a new model or open an existing example, select the target hardware, configure the required software components, prepare the Simulink model, generate code, build the application, program the target device, and debug and validate the behavior on hardware. This article is intended as an overview topic and does not replace the more detailed setup, modeling, and debugging documentation. Target Audience This article is intended for users who want to understand the overall development flow supported by the toolbox. It is useful both for new users who start from supported examples and evaluation boards and for advanced users who need to adapt the workflow to a custom target or project configuration. 4 Context Prerequisites Before following the workflow described in this article, the development environment should already be prepared. The setup process, including toolbox installation and the basic steps required to run an application, is described in the previous article. Depending on the selected project and application requirements, additional tools such as S32 Configuration Tools or EB tresos may be needed, especially when the default project configuration must be modified or when a custom project is created. Toolbox Workflow The development flow typically starts with creating a new project or opening an existing example and then selecting the target hardware. image1.png Figure 1. Opening a Simulink project or toolbox example. The selected target determines the available peripherals, supported examples, software configuration options, and build settings. As part of this step, the user can start from the default project associated with the selected target. This default project provides a ready-to-use baseline configuration and is typically the recommended option for evaluation boards and quick start development. For more advanced use cases, the workflow can also use a custom project configuration adapted to the application requirements. image2.png Figure 2. Selecting a custom project configuration. If the user continues with the default project configuration, additional low-level software changes may be limited. However, when the default project needs to be modified or when a custom project is used, tools such as S32 Configuration Tools or EB tresos may be required. image3.png Figure 3. Low-level software configuration using EB tresos or S32 Configuration Tool.  image4.png Figure 4. S32 Configuration Tool Configuration Template. Once the software stack is prepared, the Simulink model must be configured. This includes adding and parameterizing the relevant toolbox blocks, defining the application behavior, setting the model parameters, and aligning the model with the selected target and software configuration. image5.png Figure 5. Embedded Coder. image6.png Figure 6. Build or Generate Code step. After the model configuration is complete, code can be generated from the Simulink model. This step transforms the model into source code suitable for the selected target platform. The generated output reflects both the model behavior and the configuration settings applied in the previous stages. The generated code is then built using a supported compiler toolchain. The build process compiles and links the generated code together with the required software components and libraries. Build settings may vary depending on the target, compiler version, and selected optimization or debug options. image7.png Figure 7. Generated code. After a successful build, the application can be programmed onto the target hardware and executed. At this stage, the user can debug the application using the supported debug tools, inspect signals and variables, and verify that the application behaves as expected on the real hardware platform. image8.png Figure 8. Programming and debugging the application on target hardware. The final step of the workflow is validation and iteration. If issues are found during testing or debugging, the user may need to update the model, adjust the low-level software configuration, or modify build settings. The workflow is therefore iterative, allowing repeated cycles of configuration, code generation, build, programming, and validation until the desired result is achieved. Related Topics Additional details for each workflow stage are available in related documentation topics. For environment preparation, toolbox setup, and the basic steps required to run an application, refer to the previous article. More detailed information about model creation and configuration is provided in the next article. Other related topics may include examples library, supported boards and derivatives, low-level software configuration, compiler versions and options, and debugger usage. 5 References For more detailed information, refer to the related toolbox documentation and associated setup, modeling, software configuration, compiler, and debugging articles. MathWorks Simulink MathWorks Embedded Coder Generate Code from Simulink Models 6 Conclusion The toolbox workflow provides a structured path from model-based development to execution on the target hardware. Users can start quickly from the default project associated with the selected target, while still having the flexibility to create and use a custom project configuration when required. By following this workflow and using the related detailed documentation, users can iteratively configure, build, program, debug, and validate their applications more efficiently.
View full article