2392978_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2392978_en-US

2392978_en-US

Issue with Wi Fi CLI Open Thread CLI

Dear Sir,



We are using FRDM MCXW72 , to configure as OT-CLI  End node.

We tried the procedure as per document UG10349.

We are not able to go ahed after the step 5 

i.e. Run the scripts to build all examples.

$ ./script/build_mcxw72

after this command.

Please guide resolve.


FRDM-TrainingRe: Issue with Wi Fi CLI Open Thread CLI

Hello,


Hope you are doing well. MCXW72 does not support Wi-Fi, so no Wi-Fi CLI can work on this MCU.

Could you please clarify what repository and release are you using?


Best Regards,

Ricardo

Re: Issue with Wi Fi CLI Open Thread CLI

Hi,


Could you please clarify what repository and release are you using?


The log indicates that the build is failing because the Arm GCC compiler cannot be found. The compiler path being used by CMake appears to be invalid, which suggests a toolchain path configuration issue.

Could you please verify your ARMGCC_DIR configuration and confirm that arm-none-eabi-gcc is installed and accessible from that location? Once the compiler is correctly detected, the build should proceed further.


Regards,

Ricardo

Re: Issue with Wi Fi CLI Open Thread CLIWe are trying to use FRDM MCXW72 for OT CLI.
Re: Issue with Wi Fi CLI Open Thread CLI

Dear Sir,


We are trying  code FRDMRW612 _Wifi_IPv4_IPv6_Echo on FRDM RW612

Its working TCP server we are able to get the echo as per attached.

Now we are working to modify code for LED ON connected on port  GPIO 27 on FRDM

Tried to do related changes in Config Pin as well as in the file socket_task.c

We found the responce  is not coming on the terminal window after reset  but  Blue LED is glowing on FRDM board.

Please communicate the resolution on the issue.

We are not able to send the code as code size .zip is extending limit of 50Mb.


Regards

Seema Joshi


Re: Issue with Wi Fi CLI Open Thread CLI

Dear Sir,



Arm GCC compiler   path is  C:\Program Files (x86)\GNU Arm Embedded Toolchain\10 2021.10

Please let us know how to set compiler path for CMAKE.

Also please let us know about 

how to verify ARMGCC_DIR configuration and confirm that arm-none-eabi-gcc is installed and accessible from that location?



Regards

Seema Joshi






标记 (1)
无评分
版本历史
最后更新:
‎07-14-2026 03:30 AM
更新人: