Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
Anybody using Kinetis MCUs? I'm currently evaluating some USB-equipped MCUs and the Kinetis line caught my eye for its feature set. I've got a few samples (main one I'd like to focus on being the K22FN1M0VLH12), put them onto breakouts with headers and have worked out a way to bootstrap code onto them using EzPort/SPI, but I'm now getting to the point where I need to actually start proper firmware development. I've done my share of software development, but not much in the way of embedded platforms. I like the look of the new eclipse-based toolchain and Processor Expert that Freescale has released in the last few months, because it handles a lot of the peripheral initialization. However, I'm seeing a real dearth of information regarding either that or using Kinetis with a GCC-based toolchain. The only information (what little there is) going around seems to be restricted to their FRDM boards, which while cheap are restricted to a fairly small subset of their available range. Has anybody out there done any work with Kinetis recently? If so, what toolchain did you use? What are people's general impression of the Kinetis devices/documentation/tools compared to similar ARM chips from other vendors? If I get a K20 FRDM board, do people think the knowledge gained will be relatively portable to the K22F chip I'd like to use in my actual application? There is a K22F FRDM board but it is double the price, the difference being just shy of enough money to grab a STM32 dev board to evaluate alongside this. Also, in general how easy is it to port code from a dev board to a custom board? What's your approach for moving from a development board to a custom circuit? Apologies if this is a lot of questions - I'm just hoping I might be able to pick a few brains. Re: Anybody using Kinetis MCUs? Hello @lukutu , Thanks for your post.  In fact, regarding the Eclipse-based toolchain you mentioned, I assume you are referring to Kinetis Design Studio (KDS) and Processor Expert. Both of these tools are now legacy products and are no longer actively supported.  As the successor to Kinetis Design Studio, NXP introduced MCUXpresso IDE. Like KDS, MCUXpresso IDE is also Eclipse-based and integrates the GNU toolchain, SDK example import, pin/clock/peripheral configuration tools, flash programming capabilities, and seamless SDK integration, providing a more modern and fully supported development environment. MCUXPresso SDK can be download here: MCUXpresso SDK Builder You can refer to MCUXpresso Config Tool for MCUXpresso IDE for config tools usage.   As for hardware selection, I would recommend considering the FRDM-K22F board. Because it differs significantly from the K20 FRDM platform, and there is an additional benefit:  After purchase, reply to your order confirmation email to request a free FRDM-MCXE31B, FRDM-MCXN236, FRDM-MCXA153, or FRDM-MCXA156 coupon to evaluate MCX microcontrollers. Celeste_Liu_0-1783935191572.png The MCX family is NXP's latest MCU portfolio and offers a longer product lifecycle for new designs. You may want to consider the FRDM-MCXA156, which includes USB and could be a good option for future development and evaluation. About porting code from a dev board to a custom board, it's easy to realize with MCUXPresso , please refer to below posts: Hands-On Workshop: Creating a Custom Board SDK for Your Device How to Create Custom Board MCUXpresso SDK Please let me know if you have any further questions. I'd be happy to help. BR Celeste
記事全体を表示
FS26図面のソースドキュメントを請求してください。 サポートチームの皆様、   私はFS26 SBCをベースにしたソフトウェア開発に従事しています。添付の図は当社のソフトウェア開発資料に引用されていますが、元の公式文書を見つけることはできませんでした。   どのNXP FS26文書(データシート/AN/セーフティマニュアル/設計ガイド)にこの図が含まれているか、また対応する文書IDおよび図章情報の確認をご協力ください。   ご協力いただき、誠にありがとうございました。 よろしくお願いいたします。   ChandlerBing_0-1783251264458.png Re: Ask for FS26 drawing source document ライさんへ ご提供いただいた文書の抜粋は、実際には弊社のFS26文書からのものではないと思われます。代わりに、FS6500/FS4500 SBCファミリのデータシートに由来しています。 新しいFS26 SBCファミリ向けのソフトウェアを開発しているなら、代わりにFS26ソフトウェアのクイックスタートガイド(AN14492)、FS26実装と動作(AN12995)、またはFS26の完全なデータシートを調べてみてください。 BRs、トーマス Re: Ask for FS26 drawing source document トーマス様、 迅速なご説明とご指導、誠にありがとうございました! それと、もう一つデバッグに関する問題があり、ご相談させていただきたいのですが。 私たちのシステムはFS26を使ってFC7300 MCUに電源を供給しています。FS26がFS_STATES_NORMAL_FS動作状態に入った後、J-Linkを接続すると、RSTピンが連続して複数回ローにプルダウンされ、デバッガの接続が失敗します。 定期的なウォッチドッグ更新が行われる通常動作モードでは、リセットの問題は発生しません。 このマルチリセット現象の根本原因を分析し、対応するレジスタ構成やハードウェアソリューションを共有していただけますか? 改めてご支援ありがとうございます。 よろしくお願いします、 ライ ChandlerBing_0-1783330258236.png Re: Ask for FS26 drawing source document こんにちは、 JlinkとはJTAGへの接続のことでしょうか? 通常稼働しているシステムでJTAG接続時にリセットが繰り返される場合は、ウォッチドッグエラーが発生している可能性があります。 外部デバッガーがゲーム内に存在し、CPUの動作を妨害している場合、これは特に驚くべきことではない。 私たちはFS4500を使用していますが、私の記憶では、JTAGを使用する前に必ずデバッグモードを有効にしています。なぜなら、JTAG干渉中にウォッチドッグとして機能するCPU-SWスニペットが実行されていないからです。 私のささやかな理解では、デバッグモードはまさにこの目的のために作られたものだと思います。
記事全体を表示
私のS32 Design Studio for ARMバージョン2.2のライセンスが期限切れになりました。延長手続きをお願いできますでしょうか?よろしくお願いいたします。 私のS32 Design Studio for ARMバージョン2.2のライセンスが期限切れになりました。延長手続きをお願いできますでしょうか?よろしくお願いいたします。 Re: S32 Design Studio for ARM Version 2.2 许可证到期,麻烦帮忙延期,谢谢! こんにちは、 お客様のS32DSライセンスが延長されました。
記事全体を表示
i.MX95 ブートROM:eMMC Boot0/Boot1をプライマリ/セカンダリ、FlexSPI NORをリカバリとして設定する こんにちは、専門家の皆様。 i.MX95のブートROMがプライマリ、セカンダリ、リカバリーの各ブート段階をどのように処理するのかを理解しようとしています。リファレンスマニュアルやU-Bootのsplソースコードの一部は確認しましたが、リカバリーブートの仕組みがどう機能するのかはまだよく分かっていません。 私の目標は、以下のブートアーキテクチャを実装することです。 プライマリブート: eMMC Boot0 セカンダリブート: eMMC Boot1 リカバリブート: FlexSPI NORフラッシュ(ゴールデンリカバリイメージ) arch/arm/mach-imx/image-container.cを調べていると、以下のコードに気付きました: printf("Boot stage: "); if (rom_data.boot_stage == 0x6) printf("Primary\n"); else if (rom_data.boot_stage == 0x9) printf("Secondary\n"); else if (rom_data.boot_stage == 0xa) printf("Recovery\n"); else printf("USB Serial Download\n"); これに基づき、ブートROMはプライマリ、セカンダリ、リカバリー、USBシリアルダウンロードの4つのブート段階をサポートしているようです。しかし、リカバリーステージがどのように選択・設定されるのかについて十分な情報が見つかりませんでした。 以下の質問について、ご助言いただければ幸いです。 eMMC Boot0とBoot1を プライマリおよびセカンダリブートパーティションとして 使用しながら、 FlexSPI NORフラッシュをリカバリブートデバイスとして 構成することは可能ですか ? この構成がサポートされている場合、推奨される構成方法は何ですか? ブートROMがプライマリ、セカンダリ、リカバリーの各ブートステージを選択する際に従う順序は何ですか? プライマリブートとセカンダリブートの両方が失敗した場合、どのような条件でリカバリブート段階が開始されますか? 開発や検証中にリカバリーモードをシミュレートするために、意図的に再現できる故障条件はどのようなものでしょうか?  Boot ROMのブート選択アルゴリズムやリカバリーブートフローについて詳細に説明したドキュメントやアプリケーションノートはありますか? ブートデバイスのヒューズ構成(ヒューズモード) は、 リカバリブートデバイスの選択に何らかの役割を果たしますか? リカバリデバイスは、ブートデバイスのヒューズによって決定されますか? それとも、ブートROMがeMMCにフュージョンされていても、自動的に別のブートデバイス(例えばFlexSPI NORなど)に切り替わることは可能でしょうか? 最終的な目標は、システムを通常はeMMC Boot0から起動し、必要に応じてeMMC Boot1にフォールバックし、両方のeMMCブートパーティションが利用できないか無効な場合は、 FlexSPI NORに保存されているゴールデンリカバリイメージから起動することです。 もし似たようなブートアーキテクチャを実装したことがある方や、関連するドキュメントやアプリケーションノートを教えていただける方がいれば、ぜひご指導いただけるとありがたいです。 お手数ですが、よろしくお願いいたします。 BR、 アルン・クマール Re: i.MX95 Boot ROM: Configuring eMMC Boot0/Boot1 as Primary/Secondary and FlexSPI NOR as Recovery こんにちは、 eMMC Boot0とBoot1をプライマリおよびセカンダリブートパーティションとして使用しながら、 FlexSPI NORフラッシュをリカバリブートデバイスとして構成することは可能ですか? いいえ、それは不可能です。LPブート用のリカバリーブートデバイスはLPSPI1/2のみで、他のブートソースをリカバリーオプションとして設定することはできません。 Oswalag_0-1783975544422.png
記事全体を表示
Gui_GuiderはCコード生成時にフリーズする場合があります。 フォントファイルをインポートした後、生成されるCコードが途中で止まってしまいます。ページを単一サイズに縮小し、アイコンを削除してシンプルなインターフェースを作成しても、「Cコードを生成中」の状態のまま止まってしまいます。 Re: Gui_Guider在生成C code时会出现卡死的情况 Gui_Guiderに新しいフォントを直接インポートすると、Cコードの生成処理がフリーズしてしまうという問題が見つかりました。この問題を解決するにはどうすればよいでしょうか? 回复: Gui_Guider在生成C code时会出现卡死的情况 こんにちは、 @vettleさん インポートされたフォントを教えていただけますか? フォントを変更した場合も、この問題は発生しますか? BR ハリー
記事全体を表示
Wi Fi CLIのOpen Thread CLIの問題 拝啓、 私たちはFRDM MCXW72を使ってOT-CLIエンドノードとして設定しています。 私たちは文書UG10349に記載されている手順を試しました。 ステップ5以降に進むことができません つまりスクリプトを実行して、すべてのサンプルをビルドしてください。 $ ./script/build_mcxw72 このコマンドの後。 解決に向けてご指導ください。 FRDMトレーニング Re: Issue with Wi Fi CLI Open Thread CLI こんにちは、 あなたの調子が良いといいのですが。MCXW72はWi-Fiをサポートしていないため、このMCUではWi-Fi CLIは動作しません。 どのリポジトリとリリースを使っているのか、教えていただけますか? よろしくお願いいたします。 リカルド Re: Issue with Wi Fi CLI Open Thread CLI こんにちは、 どのリポジトリとリリースを使っているのか、教えていただけますか? ログを見ると、Arm GCCコンパイラが見つからないためビルドが失敗しているようです。CMakeが使用しているコンパイラパスが無効であると思われます。これは、ツールチェーンパスの設定に問題があることを示唆しています。 ARMGCC_DIRの設定を確認し、arm-none-eabi-gccがその場所からインストールされアクセス可能であることを確認していただけますか?コンパイラが正しく検出されたら、ビルドは続行されます。 よろしくお願いいたします。 リカルド Re: Issue with Wi Fi CLI Open Thread CLI OT CLIにFRDM MCXW72を使用しようとしています。 Re: Issue with Wi Fi CLI Open Thread CLI 拝啓、 FRDM RW612でコードFRDMRW612_Wifi_IPv4_IPv6_Echoを試しています 添付ファイルに示すように、正常に動作するTCPサーバーでエコーを受信することができました。 現在、FRDMのポートGPIO 27に接続されたLEDONのコードを変更する作業を進めています Config Pin と socket_task.c ファイルの両方で関連する変更を試みました。 リセット後、ターミナルウィンドウに応答が表示されませんが、FRDMボード上の青色LEDが点灯しています。 問題の解決策をお知らせください。 コードのサイズが.zipファイルで50MBの制限を超えているため、コードを送信できません。 よろしくお願いします。 シーマ・ジョシ Re: Issue with Wi Fi CLI Open Thread CLI 拝啓、 Arm GCCのコンパイラパスはC:\Program Files (x86)\GNU Arm Embedded Toolchain\10 2021.10です。 CMAKEのコンパイラパスを設定する方法を教えてください。 また、以下の点についてもお知らせください。 ARMGCC_DIR設定を確認し、その場所からarm-none-eabi-gccがインストールされアクセス可能であることをどうやって確認すればいいですか? よろしくお願いします。 シーマ・ジョシ
記事全体を表示
S32 Design Studio for ARM v2.2 ライセンス拡張版 こんにちは。S32 Design Studio for ARM v2.2のインストールにおけるアクティベーション期間の延長についてサポートをお願いします。アクティベーションコードはFAF2-FCC2-8A8E-87ACです。よろしくお願いいたします。 こんにちは。S32 Design Studio for ARM v2.2のインストールにおけるアクティベーション期間の延長についてサポートが必要です。アクティベーションコード:FAF2-FCC2-8A8E-87AC。ありがとうございます! Re: S32 Design Studio for ARM v2.2许可延期 こんにちは、 お客様のライセンス期間を延長いたしました。 よろしくお願いいたします。 ピーター
記事全体を表示
i.MX8M Plus - SD2_VSELは3.3Vに固定されています チームの皆さん、こんにちは。 SD2の電圧は3.3Vである必要があります。設計に1.8Vは入れたくありません。 では、PDをSD_VSEL(PMICピン)に入れて電圧を3.3Vに固定することはできますか? また、SoCからGPIOピンを1つ保存することもできます ハードウェアコントロールを進めて、ソフトウェアコントロールは提供されませんか? i.MX 8ファミリ | i.MX 8QuadMax (8QM) | 8QuadPlus Re: i.MX8M Plus - SD2_VSEL fixed at 3.3V こんにちは、@ramkrish。 NXPサポートにご連絡いただきありがとうございます! EVKでは、SDカードの電圧切り替え信号がプロセッサのGPIOに接続されています。 SDドライバーはカード初期化および交渉の過程で自動的に3.3Vと1.8Vを切り替えます。高速microSDカードが検出され、カードとホストの両方が低電圧動作をサポートしている場合、ドライバーは1.8V信号に移行し、高性能モードを有効にします。 必要に応じてSDインターフェース電圧を手動で調整することもできます。しかし、このシステムは、動作条件に応じて電圧変動を自動的に処理するように既に設計されている。 よろしくお願いします、 チャビラ
記事全体を表示
s32k 148 LED 闪烁示例代码 您好,我正在使用S32K148 LED闪烁示例代码,但在调试时遇到了问题。我会分享错误截图。请检查一下,并告诉我可能的原因以及代码中需要做哪些更改。 dipalipatil21212313_0-1783745336347.png dipalipatil21212313_1-1783745344796.png Re: s32k 148 Led Blinking example code 你好 我在 S32DS v3.4 中调试S32K1 SDK RTM 4.0.3的ftm_periodic_interrupt_s32k148项目时没有遇到这个问题。 请告诉我如何重现这个问题,例如您做了哪些修改。如果方便的话,请上传修改后的程序,以便我能快速排查 S32K148EVB 的问题原因。 此致敬礼, Robin
記事全体を表示
eTPU crank, cam, injections and Ignitions on S32K3 Hello, I need to implement drivers to actuate Injections and ignitions phased with crank and cam signals. I need to understand which is the best solution to implement this drivers. My doubt are: 1) The API provided by AN4907SW.zip are compatible with eTPU present in S32K3xx? 2)If no, it's a good solution adapt this API for S32K3xx or the best solution it's use ConfigTool ? There is an example for S32K3xx about this application? Regards, Francesco. Re: eTPU crank, cam, injections and Ignitions on S32K3 Hi @francescovico  Converting data from big-endian to little-endian involves reversing the byte order by adjusting bit shifts and masks according to the data type size. GCC provides built-in functions to simplify this process, for example: uint32_t __builtin_bswap32 (uint32_t x). You can find more details in the GCC documentation: 7.2.3 Byte-Swapping Builtins Re: eTPU crank, cam, injections and Ignitions on S32K3 Hi @VaneB , if I understood well , the Automotive functions (CRANK, SPARK...), are made for big endian microcontrollers. To use eTPU with Automotive functions on S32K364 (little endian), I need to download a function set selecting : francescovico_0-1761136257258.png And change the functions: uint32_t *fs_memcpy32(uint32_t *dest,uint32_t *source,uint32_t size); void fs_memset32(uint32_t *start,uint32_t value,int32_t size); to swap each 32 bit values to read/write little endian code and parameters, it's true? Regards, Francesco. Re: eTPU crank, cam, injections and Ignitions on S32K3 Hi @francescovico  The S32K39/37/36 Microcontrollers for Electrification Applications, includes eTPU. However, there is currently no dedicated documentation or demo similar to the MPC5634's AN4907 available for these devices. That said, the AN4907 document, demo, and microcode are suitable for the S32K39/37/36 family, but please note that these devices use a little-endian architecture. Therefore, you will need to modify the memory access API. You can refer to the motor control-related modules in the CodeWarrior eTPU Function Selector, which has been updated to little-endian. BR, VaneB Re: eTPU crank, cam, injections and Ignitions on S32K3 Thanks for pointing this out! There was an endianity conversion issue. As a result, the missing tooth mask was not configured correctly and it counted 350 deg per rev resp 700 deg per cycle. Now, the demo app in the original post is fixed. Re: eTPU crank, cam, injections and Ignitions on S32K3 Hi @MilanBrejl , Now I'm trying to use Fuel Cyl 1 etpu driver. It seem that  the driver use s24AngleNormalEnd as "start angle" and stop all injections at s24AngleStop. The duration u24InjectionTime it's never respected. It's possible? Attached there is a .rar file that contain  picoscope acquisition of "fuel cyl 1" where the injector parameter are: Etpu_Fuel_Ip_ConfigType fuel_1_config = { .s24AngleNormalEnd = DEG2TCR2(-180), .s24AngleStop = DEG2TCR2(-360), .s24AngleOffsetRecalc = DEG2TCR2(-30), .u24InjectionTime = USEC2TCR1(1200), .u24CompensationTime = USEC2TCR1(0), .u24InjectionTimeMinimum = USEC2TCR1(0), .u24OffTimeMinimum = USEC2TCR1(0), .eGenerationDisable = ETPU_FUEL_GENERATION_ALLOWED }; In the picoscope acquisition it's visible start of injection exactly at 180° , stop of injection at 360° and injection duration of 30 ms (it should be 1,2ms). Regards, Francesco. Re: eTPU crank, cam, injections and Ignitions on S32K3 Hi @MilanBrejl  , Now I'm trying to use Fuel Cyl 1 etpu driver. It seem that  the driver use s24AngleNormalEnd as "start angle" and stop injection ever at s24AngleStop. The duration u24InjectionTime it's never respected. It's possible? Attached there is a .rar file that contain  picoscope acquisition of "fuel cyl 1" where the injector parameter are: Etpu_Fuel_Ip_ConfigType fuel_1_config = { .s24AngleNormalEnd = DEG2TCR2(-180), .s24AngleStop = DEG2TCR2(-360), .s24AngleOffsetRecalc = DEG2TCR2(-30), .u24InjectionTime = USEC2TCR1(1200), .u24CompensationTime = USEC2TCR1(0), .u24InjectionTimeMinimum = USEC2TCR1(0), .u24OffTimeMinimum = USEC2TCR1(0), .eGenerationDisable = ETPU_FUEL_GENERATION_ALLOWED }; In the picoscope acquisition it's visible start of injection exactly at 180° , stop of injection at 360° and injection duration of 30 ms (it should be 1,2ms). Regards, Francesco. Re: eTPU crank, cam, injections and Ignitions on S32K3 Hi @MilanBrejl , You are right, the s24AngleOffsetRecalc must be a positive number, but putting: s24AngleOffsetRecalc = DEG2TCR2(30) The result it's the same (. I'm using S32K364 that have 2 ETPU (A and B) with 16 channels. Using fuel driver on ETPUA the driver work correctly, but I need to use ETPUB channel 0. My necessity it's to share TCR1 and TCR2 from ETPUA to ETPUB, using STAC registers. It's possible that STAC registers are not correctly initialized? Regards, Francesco. Re: eTPU crank, cam, injections and Ignitions on S32K3 Hi @francescovico, this is how to configure STAC_ENG1 and STAC_ENG2 registers to share TCR1 and TCR2 from eTPU1 to eTPU2: MilanBrejl_0-1770199430269.png Let me know if it helps.  Regards, Milan Re: eTPU crank, cam, injections and Ignitions on S32K3 Hi @MilanBrejl , my registers are exactly the same of your suggestion: ETPU_A_B_REGISTER.png But the problem it's still present. In the attached picoscope acquisition you can see the spark generated with ETPU A in BLU and spark generated with ETPU B in RED. Both sparks have end angle 180 degree and dwell time 8000 us. Regards, Francesco.   Re: eTPU crank, cam, injections and Ignitions on S32K3 Hi @francescovico, I duplicated your issue on my site and found the root cause. It is not enough to share TCR1/TCR2 time/angle buses between both eTPU engines. Spark and Fuel functions do time to angle transformation, based on the actual engine speed. It uses TRR (Tick Rate Register). This register is part of the Angle Clock logic and it is maintained by Crank eTPU function, running on eTPU A. Hence, TRR has the correct value on eTPU A only. Then, time to angle transformation on eTPU B, using eTPU B TRR, returns a wrong result. This is pretty fundamental, I probably never met anybody running engine control over both eTPU engines and hence this has not been solved. And especially with the new S32K3 devices limited to 16+16 channels this becomes important. Thanks for bringing up this use-case and thanks for your patience. The attached demo application is based on the previous one (in this thread) and adds the following changes: Spark 2 channel is moved from eTPU engine A to eTPU engine B MilanBrejl_0-1770672522362.png Channel masks are updated accordingly MilanBrejl_1-1770672675064.png Channel links need to support usage of both engines (use macro ETPU_IP_CHANNEL_TO_LINK) MilanBrejl_2-1770672729220.png pin configuration is updated, interrupt configuration updated And now new features of Crank eTPU FW: eTPU FW image is updated. The Crank function can run on both engines and update the TRR value also for the other eTPU engine.  This new feature requires to set one new parameter to the Crank configuration MilanBrejl_4-1770673143063.png where MilanBrejl_3-1770673103441.png I hope this helps.  Regards, Milan Re: eTPU crank, cam, injections and Ignitions on S32K3 Hi @MilanBrejl , Now It's working perfectly. Thank you very much for the support! Regards, Francesco. Re: eTPU crank, cam, injections and Ignitions on S32K3 Hello, I'm also researching the K396 board and want to use ETPU for crankshaft, camshaft, and oil injectors. Could we discuss this further?
記事全体を表示
#S32K312 IO input config joshua9264_0-1783597102225.png I want to used LPUART0 RX,need config IMCR[699],but spec only IMCR[473],So ,what should I do ? Re: #S32K312 IO input config Hi @joshua9264  It is noted in Section 10.1.2 of the S32K3xx Reference Manual, Rev. 12, that: "IMCRs defined in the attached IOMUX file have an offset of 512 with respect to the IMCR number defined in SIUL2 memory map section." To help clarify how the offset is applied, an example is also provided in Section 4.4.3 of the RM. BR, VaneB Re: #S32K312 IO input config yes,I found it. thank you
記事全体を表示
#S32K312 IO入力設定 joshua9264_0-1783597102225.png LPUART0 RXを使用したいのですが、IMCR[699]を設定する必要がありますが、仕様にはIMCR[473]しかありません。どうすればよいでしょうか? Re: #S32K312 IO input config こんにちは、@joshua9264さん S32K3xxリファレンスマニュアル改訂版12のセクション10.1.2には次のように記されています。 「添付のIOMUXファイルで定義されているIMCRは、SIUL2メモリマップセクションで定義されているIMCR番号に対して512のオフセットを持っています。」 オフセットの適用方法を明確にするために、RMのセクション4.4.3にも例が記載されています。 BR、VaneB Re: #S32K312 IO input config はい、見つけました。ありがとう
記事全体を表示
i.MX8M Plus - SD2_VSEL 固定为 3.3V 大家好, 我需要SD2电压为3.3V。我的设计中不需要1.8V。 那么我可以将PD放置在SD_VSEL(PMIC引脚)上,使电压固定在3.3V吗? 此外,我还可以从SoC中节省一个GPIO引脚。 只进行硬件控制而不进行软件控制是否可以? i.MX 8 系列 | i.MX 8QuadMax (8QM) | 8QuadPlus Re: i.MX8M Plus - SD2_VSEL fixed at 3.3V 嗨@ramkrish , 感谢您联系恩智浦技术支持! 在 EVK 上,SD 卡电压开关信号连接到处理器的 GPIO。 SD 驱动程序在卡初始化和协商过程中自动在 3.3V 和 1.8V 之间切换。如果检测到高速 microSD 卡,并且该卡和主机都支持较低电压运行,则驱动程序将切换到 1.8V 信号以启用更高性能模式。 如有需要,您也可以手动控制 SD 接口电压。但是,该系统已经设计成可以根据运行条件自动处理电压转换。 此致, 查维拉
記事全体を表示
S32 Design Studio for ARM v2.2许可延期 您好,S32 Design Studio for ARM v2.2,Activation Code:FAF2-FCC2-8A8E-87AC,麻烦帮我延期,谢谢! Hello, I need help extending the activation period for my S32 Design Studio for ARM v2.2 installation. Activation Code: FAF2-FCC2-8A8E-87AC. Thank you! Re: S32 Design Studio for ARM v2.2许可延期 你好, 我们已延长您的许可证期限。 顺祝商祺! Peter
記事全体を表示
Clarification Required on ECC Support for External Memory Interfaces in MIMXRT1170 and MIMXRT1180 Hello NXP Team, We are evaluating the MIMXRT1170 and MIMXRT1180 for a critical application where memory integrity is a key requirement. As a result, understanding the exact ECC coverage on these devices is very important for our architecture and device selection process. After reviewing the available documentation, we were unable to find a clear summary of which external memory interfaces provide ECC protection and how that ECC is implemented. 1. External Interface ECC Coverage For both MIMXRT1170 and MIMXRT1180, which of the following interfaces support ECC? FlexSPI NOR Flash FlexSPI HyperFlash FlexSPI HyperRAM SEMC SDRAM SEMC SRAM/PSRAM eMMC SD Card Interface Other external memory interfaces (if applicable) 2. ECC Implementation For each supported interface: Is ECC provided natively by the hardware controller? Is ECC automatically active in hardware, or does it require software configuration? 3. XECC Usage (RT1170) The Reference Manual discusses the XECC module; however, it is not completely clear how it relates to external memories. Could you clarify: Which memories/interfaces can be protected through XECC? Is XECC intended only for internal memories, or can it also protect data stored in external SDRAM, SRAM, HyperRAM, Flash, etc.? Are there any usage examples or application notes demonstrating XECC protection for external memory interfaces? Regards, Pooja Re: Clarification Required on ECC Support for External Memory Interfaces in MIMXRT1170 and MIMXRT118 i.MX RT1170 ECC Application You can refer to the AN13204 for ECC enablement. ECC mainly for internal memory, For external memory, ECC is mainly for NAND device both parallel and serial. You can check UM for detailed information. What kind of memory do you want to use for ECC? Re: Clarification Required on ECC Support for External Memory Interfaces in MIMXRT1170 and MIMXRT118 Hi @Pooja_04 , Thank you for your questions! 1. External Interface ECC Coverage MIMXRT1170 The FlexSPI and SEMC controllers do not themselves provide generic native ECC for the external memory data path. However, the RT1170 integrates three independent External ECC Controller (XECC) instances, associated respectively with FlexSPI1, FlexSPI2, and SEMC. eMMC and SD Card (via uSDHC) have no MCU-side ECC. MIMXRT1180 The currently available product documentation explicitly specifies hardware ECC for the SEMC Raw NAND interface. It does not specify generic controller-side ECC for SEMC SDRAM/SRAM, FlexSPI NOR/HyperFlash/HyperRAM, or SD/eMMC, and the RT1180 documentation does not identify the RT1170-style XECC_FLEXSPI / XECC_SEMC modules. eMMC/SD devices may implement internal media ECC, and the SD/eMMC protocol uses CRC for transfer-error detection, but these mechanisms should not be treated as MCU-side end-to-end ECC protection. 2. ECC Implementation MIMXRT1170 — XECC (external memories): ECC is not provided natively by the FlexSPI/SEMC controllers; it is provided by the dedicated XECC modules. ECC is not enabled automatically. Software (or the applicable ROM/fuse flow, via fuse) must configure the ECC address regions and enable read/write ECC processing. Each XECC instance supports four configurable protected address windows, and it expands each 32-bit data word with 32 bits of ECC. The complete region must be initialized (preloaded) before it is read; otherwise reads will raise ECC errors.  MIMXRT1180 — SEMC NAND hardware ECC: Provided natively by the SEMC controller hardware for the Raw NAND interface (8/16-bit). 3. XECC Usage (RT1170) XECC is intended for external memories. It is not for internal memories — internal TCM/Cache/OCRAM use separate ECC mechanisms (core-built-in ECC and the FlexRAM/MECC controllers). XECC can protect data in external SDRAM, SRAM/PSRAM (behind SEMC) and NOR Flash / HyperFlash / HyperRAM (behind FlexSPI1/FlexSPI2). Usage examples / documentation: AN13204 — "i.MX RT1170 ECC Application" (covers XECC for external memory, fuse/software configuration, ROM preload, error injection): https://www.nxp.com/docs/en/application-note/AN13204.pdf (companion code: AN13204SW) MCUXpresso SDK XECC examples (RT1170/RT1160 only) i.MX RT1170 Reference Manual (IMXRT1170RM) — dedicated XECC chapter. Thus, if ECC protection of external SDRAM/SRAM or FlexSPI Flash/HyperRAM is a hard requirement for your critical application, the RT1170 (via XECC) meets this, whereas the RT1180 does not provide an equivalent external-ECC controller — on the RT1180, controller-side external ECC is limited to the SEMC Raw NAND interface. Best regards, Gavin
記事全体を表示
SPI communication failed in DMA mode(S32k328) 在调用Rm_Init(&Rm_Config);函数后再串口输出就会出现硬件错误错误。 注释掉Rm_Init(&Rm_Config),调用  显示状态一直为busy,我只列出了关键的初始化函数。 if (Lpspi5_ready_flag == 0u) { spi_status = Lpspi_Ip_AsyncTransmit(&LPSPI5_EXTERNAL_DEVICE, &Spi5TxBuffer[0], &Spi5RxBuffer[0], NUMBER_OF_BYTES, Spi5_EndCallback); if (spi_status != LPSPI_IP_STATUS_SUCCESS) { printf("SpiTp: AsyncTransmit FAIL\r\n"); return; } } static void system_init(void) { /* Initialize Clock */ Clock_Ip_StatusType Status_Init_Clock = CLOCK_IP_ERROR; Status_Init_Clock = Clock_Ip_Init(Clock_Ip_aClockConfig); /* Initialize all pins using the Port driver */ Siul2_Port_Ip_PortStatusType Status_Init_Port = SIUL2_PORT_ERROR; Status_Init_Port = Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS_PortContainer_0_BOARD_InitPeripherals, g_pin_mux_InitConfigArr_PortContainer_0_BOARD_InitPeripherals); /* Initialize interrupt */ IntCtrl_Ip_Init(&IntCtrlConfig_0); /* Initialize Dma */ IntCtrl_Ip_EnableIrq(DMATCD0_IRQn); IntCtrl_Ip_EnableIrq(DMATCD1_IRQn); Dma_Ip_Init(&Dma_Ip_xDmaInitPB); Dma_Mux_Ip_Init(&Dma_Mux_Config); //Rm_Init(&Rm_Config); } /* Initialize each Spi hardware units using*/ Lpspi_Ip_Init(&Lpspi_Ip_PhyUnitConfig_SpiPhyUnit_0_Instance_4); Lpspi_Ip_Init(&Lpspi_Ip_PhyUnitConfig_SpiPhyUnit_1_Instance_5); Lpspi_Ip_Init(&Lpspi_Ip_PhyUnitConfig_SpiPhyUnit_2_Instance_3); /* Update Framesize */ Lpspi_Ip_UpdateFrameSize(&LPSPI4_EXTERNAL_DEVICE, 8U); Lpspi_Ip_UpdateFrameSize(&LPSPI5_EXTERNAL_DEVICE, 8U); Lpspi_Ip_UpdateFrameSize(&LPSPI3_EXTERNAL_DEVICE, 8U); /* Update Transfered Bit order */ Lpspi_Ip_UpdateLsb(&LPSPI4_EXTERNAL_DEVICE, TRUE); Lpspi_Ip_UpdateLsb(&LPSPI5_EXTERNAL_DEVICE, TRUE); Lpspi_Ip_UpdateLsb(&LPSPI3_EXTERNAL_DEVICE, TRUE); /* Update Transfer Mode */ Lpspi_Ip_UpdateTransferMode(LPSPI4_EXTERNAL_DEVICE.Instance, LPSPI_IP_INTERRUPT); Lpspi_Ip_UpdateTransferMode(LPSPI5_EXTERNAL_DEVICE.Instance, LPSPI_IP_INTERRUPT); Lpspi_Ip_UpdateTransferMode(LPSPI3_EXTERNAL_DEVICE.Instance, LPSPI_IP_INTERRUPT); /* SPI5 AsyncTransmit 完成回调 */ static void Spi5_EndCallback(uint8 Instance, Lpspi_Ip_EventType Event) { (void)Instance; if (Event == LPSPI_IP_EVENT_END_TRANSFER) { Spi5TransferOk = TRUE; Spi5TransferFault = FALSE; } else /* LPSPI_IP_EVENT_FAULT */ { Spi5TransferFault = TRUE; Spi5TransferOk = FALSE; } Spi5TransferDone = TRUE; } Re: SPI communication failed in DMA mode(S32k328) hi,@VaneB  根据你的回复我更改了RM 配置DMAMUX 源为通道16和通道17,并且DMA也是对应的通道16和通道17。 1.我注释掉 Rm_Init(&Rm_Config); 保留 Dma_Mux_Ip_Init(&Dma_Mux_Config); 中断能够正常的触发。 2.我注释掉 Dma_Mux_Ip_Init(&Dma_Mux_Config); 保留 Rm_Init(&Rm_Config); 还是会触发硬件错误。 现在已经能够正常使用,要是能解决这个问题那就更完美了,非常感谢! BR, zyzzzz Re: SPI communication failed in DMA mode(S32k328) 嗨@zyzzzz 关于您的配置,我有一些意见。您已将 LPSPI5 配置为使用 DMA;但是,在 RM 配置中,分配给通道 0 和通道 1 的 DMA MUX 源对应于 LPSPI_1,而不是 LPSPI_5。 另外,如果您已经在拨打电话: Dma_Mux_Ip_Init(&Dma_Mux_Config); 无需再拨打电话: Rm_Init(&Rm_Config); 反之亦然。这是因为 Rm_Init() 内部执行以下初始化序列: Rm_Init() └─ Rm_InitGroup1() └─ Rm_Ipw_Dma_Mux_Init() └─ Dma_Mux_Ip_Init() 因此,DMA MUX 被初始化了两次。我建议只保留一个初始化函数。 BR,VaneB Re: SPI communication failed in DMA mode(S32k328) 嗨@zyzzzz 我注意到您正在使用 DMAMUX0 配置 DMA 通道。但是,如果您参考参考手册中包含的 S32K3xx_DMAMUX_map.xlsx 文件,您可以验证 LPSPI_5 DMA 请求映射到 DMAMUX1,而不是 DMAMUX0。 请更新配置,使用 DMAMUX 实例 1 而不是实例 0。 Re: SPI communication failed in DMA mode(S32k328) Hi, @VaneB  很高兴收到你的回复,我明白了你的意思,但是现在不能选择DMAMUX instance 1。 在选择DMA_INSTANCE_0的前提下,选择Dma Hardware Channel 16,就能选择Dma Mux Source为DMA_MUX_1_LPSPI_5_TX_REQUEST。
記事全体を表示
S32K3 上的 eTPU 曲柄、凸轮、喷射和点火装置 你好 我需要执行驱动程序,以根据曲柄和凸轮信号相位启动喷油和点火装置。 我需要了解实施该驱动程序的最佳解决方案是什么。 我的疑问是 1) AN4907SW.zip 提供的 API 是否与 S32K3xx 中的 eTPU 兼容? 2)如果不是,那么将此 API 用于 S32K3xx 是一个好的解决方案,还是使用 ConfigTool 才是最佳解决方案? S32K3xx 有关于此应用的示例吗? 敬请期待,弗朗切斯科。 Re: eTPU crank, cam, injections and Ignitions on S32K3 你好@francescovico 将数据从大端转换为小端序涉及通过根据数据类型大小调整位移和掩码来反转字节顺序。 GCC 提供了内置函数来简化这个过程,例如:uint32_t __builtin_bswap32 (uint32_t x)。你可以在 GCC 文档中找到更多细节:7.2.3 字节交换内置函数 Re: eTPU crank, cam, injections and Ignitions on S32K3 你好@VaneB、 如果我理解得不错,汽车功能(CRANK、SPARK......)是为大位微控制器设计的。 要在 S32K364(小二进制)上使用带有汽车功能的 eTPU,我需要下载一个功能集,选择 .NET 和 .NET: francescovico_0-1761136257258.png 并更改功能: uint32_t *fs_memcpy32(uint32_t *dest,uint32_t *source,uint32_t size); void fs_memset32(uint32_t *start,uint32_t value,int32_t size); 交换每个 32 位的值,以读取/写入小端代码和参数,是这样吗? 敬请期待,弗朗切斯科。 Re: eTPU crank, cam, injections and Ignitions on S32K3 你好@francescovico 用于电气化应用的 S32K39/37/36 微控制器包括 eTPU。但是,目前没有适用于这些设备的与 MPC5634 的 AN4907 相似的专用文档或演示。 也就是说,AN4907 文档、演示和微码适用于 S32K39/37/36 系列,但请注意,这些设备使用小端架构。因此,您需要修改内存访问 API。 您可以参考 CodeWarrior eTPU 功能选择器 中与电机控制相关的模块,该功能 选择器 已更新为 little-endian。 BR、VaneB Re: eTPU crank, cam, injections and Ignitions on S32K3 感谢您指出这一点! 这是个endianity转换问题。因此,缺齿掩模的配置不正确,每转 350 度,每周期 700 度。 现在,原帖中的演示程序已经修复。 Re: eTPU crank, cam, injections and Ignitions on S32K3 你好@MilanBrejl、 现在,我正在尝试使用 Fuel Cyl 1 etpu 驱动程序。 驱动程序似乎使用 s24AngleNormalEnd 作为"的起始角度" ,并在 s24AngleStop 停止注入。 u24InjectionTime 的持续时间永远不会被遵守。 有可能吗? 附件中有一个 .rar 文件该文件包含"燃料缸 1" 的 picoscope 采集信息,其中喷油器参数为: Etpu_Fuel_Ip_ConfigType fuel_1_config = { .s24AngleNormalEnd= DEG2TCR2(-180), .s24AngleStop= DEG2TCR2(-360), .s24AngleOffsetRecalc= DEG2TCR2(-30), .u24InjectionTime= USEC2TCR1(1200), .u24CompensationTime= USEC2TCR1(0), .u24InjectionTimeMinimum= USEC2TCR1(0), .u24OffTimeMinimum= USEC2TCR1(0), .eGenerationDisable= etpu_fuel_generation_allowed }; 在 picoscope 采集器中,可以看到注入开始点正好是 180°,注入停止点是 360°,注入持续时间为 30 毫秒(应为 1.2 毫秒)。 敬请期待,弗朗切斯科。 Re: eTPU crank, cam, injections and Ignitions on S32K3 你好@MilanBrejl、 现在,我正在尝试使用 Fuel Cyl 1 etpu 驱动程序。 驱动程序似乎使用s24AngleNormalEnd 作为"的起始角度" ,并在 s24AngleStop 停止所有注入。 u24InjectionTime 的持续时间永远不会被遵守。 有可能吗? 附件中有一个 .rar 文件文件,其中包含喷油器参数所在的"燃油 1 缸" 的 picoscope 采集结果: Etpu_Fuel_Ip_ConfigType fuel_1_config = { .s24AngleNormalEnd= DEG2TCR2(-180), .s24AngleStop= DEG2TCR2(-360), .s24AngleOffsetRecalc= DEG2TCR2(-30), .u24InjectionTime= USEC2TCR1(1200), .u24CompensationTime= USEC2TCR1(0), .u24InjectionTimeMinimum= USEC2TCR1(0), .u24OffTimeMinimum= USEC2TCR1(0), .eGenerationDisable= etpu_fuel_generation_allowed }; 在 picoscope 采集器中,可以看到注入开始点正好是 180°,注入停止点是 360°,注入持续时间为 30 毫秒(应为 1.2 毫秒)。 敬请期待,弗朗切斯科。 Re: eTPU crank, cam, injections and Ignitions on S32K3 你好@MilanBrejl、 你说得没错,s24AngleOffsetRecalc 必须是正数,但要把它放进去: s24AngleOffsetRecalc = DEG2TCR2(30) 结果还是一样(......)。 我使用的 S32K364 有 2 个 ETPU(A 和 B),共 16 个通道。 在 ETPUA 上使用燃料驱动程序,驱动程序工作正常,但我需要使用 ETPUB 通道 0。 我需要使用 STAC 寄存器将 TCR1 和 TCR2 从 ETPUA 共享到 ETPUB。 可能是 STAC 寄存器没有正确初始化? 敬请期待,弗朗切斯科。 Re: eTPU crank, cam, injections and Ignitions on S32K3 你好@francescovico, 这是如何配置 STAC_ENG1 和 STAC_ENG2 寄存器,以便从 eTPU1 到 eTPU2 共享 TCR1 和 TCR2: MilanBrejl_0-1770199430269.png 如果有帮助,请告诉我。 致: Milan Re: eTPU crank, cam, injections and Ignitions on S32K3 你好@MilanBrejl、 我的注册表与您的建议完全相同: ETPU_A_B_REGISTER.png 但问题依然存在。 在所附的皮镜采集中,您可以看到 ETPU A 产生的火花为蓝色,ETPU B 产生的火花为红色。 两个火花的端角都是 180 度,停留时间都是 8000 秒。 敬请期待,弗朗切斯科。   Re: eTPU crank, cam, injections and Ignitions on S32K3 你好,@francescovico、 我在我的网站上复制了你的问题,并找到了根本原因。在两个 eTPU 引擎之间共享 TCR1/TCR2 时间/角度总线是不够的。火花和燃油功能根据发动机的实际转速进行时间到角度的转换。它使用 TRR(跳动速率寄存器)。该寄存器是角度时钟逻辑的一部分,由运行在 eTPU A 上的 Crank eTPU 功能维护。然后,使用 eTPU B TRR 对 eTPU B 进行时间到角度的变换会返回错误的结果。 这是最基本的问题,我可能从未见过有人同时在两个 eTPU 引擎上运行引擎控制,因此这个问题一直没有得到解决。尤其是在新的 S32K3 设备仅限于 16+16 个通道的情况下,这一点变得很重要。感谢您提出这个用例,也感谢您的耐心。 所附的演示程序以之前的程序(在本主题中)为基础,并增加了以下改动: 火花 2 通道从 eTPU 引擎 A 移至 eTPU 引擎 B MilanBrejl_0-1770672522362.png 相应更新通道掩码 MilanBrejl_1-1770672675064.png 通道链接需要支持两个引擎的使用(使用宏 ETPU_IP_CHANNEL_TO_LINK) MilanBrejl_2-1770672729220.png 引脚配置已更新,中断配置已更新 现在是 Crank eTPU FW 的新功能: 更新 eTPU FW 映像。曲柄功能可在两个发动机上运行,并更新另一个 eTPU 发动机的 TRR 值。 这项新功能需要在曲柄配置中设置一个新参数 MilanBrejl_4-1770673143063.png 其中 MilanBrejl_3-1770673103441.png 希望对您有所帮助。 致: Milan Re: eTPU crank, cam, injections and Ignitions on S32K3 你好@MilanBrejl、 现在它工作得很好。 非常感谢你们的支持! 敬请期待,弗朗切斯科。 Re: eTPU crank, cam, injections and Ignitions on S32K3 您好,我也在研究k396的板子,也想将etpu用于曲轴凸轮轴和喷油,我们可以交流一下嘛
記事全体を表示
s32k 148 Led Blinking example code Hi, I am using the S32K148 LED blinking example code, but I am facing an issue while debugging it. I will share a screenshot of the error. Please check it and let me know the possible reason and what changes are required in the code. dipalipatil21212313_0-1783745336347.png dipalipatil21212313_1-1783745344796.png Re: s32k 148 Led Blinking example code Hi  I didn't encounter this problem when debugging the ftm_periodic_interrupt_s32k148 project of S32K1 SDK RTM 4.0.3 in S32DS v3.4. Please tell me how to reproduce this problem, such as what modifications you made. If convenient, please upload the modified program so I can quickly troubleshoot the cause on S32K148EVB. Best Regards, Robin
記事全体を表示
s32k 148個のLED点滅サンプルコード こんにちは。S32K148 LED点滅のサンプルコードを使用しているのですが、デバッグ中に問題が発生しています。エラー画面のスクリーンショットを共有します。ご確認いただき、考えられる原因とコードに必要な変更点をお知らせください。 dipalipatil21212313_0-1783745336347.png dipalipatil21212313_1-1783745344796.png Re: s32k 148 Led Blinking example code こんにちは S32DS v3.4でS32K1 SDK RTM 4.0.3のftm_periodic_interrupt_s32k148プロジェクトをデバッグした際にはこの問題に遭遇しませんでした。 この問題の再現方法、例えばどのような変更を加えたかなどを教えてください。もしよければ、修正したプログラムをアップロードしてください。S32K148EVBで原因を素早く確認できます。 よろしくお願いいたします ロビン
記事全体を表示
LS1088A 上的 DDRv 工具存在问题 您好,我正在尝试在基于 LS1088A SoC 的定制板上验证一种新型 DDR4 SO-DIMM,但我遇到了 DDRv 问题。我之前已经验证过其他几款DDR4内存,没有遇到任何问题。 我正在尝试验证的新型 DDR 芯片是来自 Memphis 的 IMM2G72D4SOD8AG-B075I。它的速度等级为 2,666,但我们希望它的运行速度为 2,100 MT/s。我创建了一个新的 QorQ 配置项目,并通过 SPD 成功读取了 DDR 配置。然而,第一步(时钟居中)在“自动搜索和检测写入均衡起始值”部分始终以 0.04% 的失败率失败。 在测试结果摘要中,我看到测试失败,原因是:“DDR接口故障并非由WRLVL_START值引起,请检查板上的硬件问题。 ” 在“日志”部分,我看到以下信息: ################## ## Result for: wrlvl_searcher ## ## ## Run  1 ## ####################################   测试结果:[ ============================================================ 已更新:WRLVL_CNTL = 0x86550605,WRLVL_CNTL_2 = 0x00000000,WRLVL_CNTL_3 = 0x00000000,SDRAM_CLK_CNTL = 0x02800000     ============================================================ 已更新:WRLVL_CNTL = 0x86550607,WRLVL_CNTL_2 = 0x09060C0F,WRLVL_CNTL_3 = 0x0E110B0E,SDRAM_CLK_CNTL = 0x02800000     ============================================================ 已更新:WRLVL_CNTL = 0x86550607,WRLVL_CNTL_2 = 0x09050C0F,WRLVL_CNTL_3 = 0x1611130E,SDRAM_CLK_CNTL = 0x02800000     DDR接口故障并非由于WRLVL_START值的问题,请检查主板上的硬件问题。 测试失败! {{DDR interface is failing due to an issue other than WRLVL_START values, please investigate HW issues on the board.}}     错误捕获寄存器: 0xE20, 0x00000000 0xE24, 0x00000000 0xE28, 0x00000000 0xE40, 0x00000080 0xE44, 0x00000000 0xE48, 0x0000001D 0xE4C, 0x00000000 0xE50, 0x00000000 0xE54, 0x00000000 0xE58, 0x00010000     倾倒: 0xF00, 0x00000000 0xF04, 0x00001002 0xF08, 0x0000000A 0xF0C, 0x14000C20 0xF10, 0x00000000 0xF14, 0x00000000 0xF18, 0x00000000 0xF1C, 0x00000000 0xF20, 0x00000000 0xF24, 0x2F003500 0xF28, 0x2A003600 0xF2C, 0x3E004A00 0xF30, 0x44004600 0xF34, 0x3A007000 0xF38, 0x00000000 0xF3C, 0x00000000 0xF40, 0x00000000 0xF44, 0x00000000 0xF48, 0x00000001 0xF4C, 0x94000000 0xF50, 0x0F001300 0xF54, 0x0C001800 0xF58, 0x1F002C00 0xF5C, 0x22002700 0xF60, 0x1C000000 0xF64, 0x00009000 0xF68, 0x00000020 0xF6C, 0x00000000 0xF70, 0x0060007B 0xF74, 0x00000000 0xF78, 0x00000000 0xF7C, 0x00000000 0xF80, 0x00000000 0xF84, 0x00000000 0xF88, 0x00000000 0xF8C, 0x00000000 0xF90, 0x00000000 0xF94, 0x80000000 0xF98, 0x00000000 0xF9C, 0x29002B00 0xFA0, 0x2B002B00 0xFA4, 0x27002D00 0xFA8, 0x28002E00 0xFAC, 0x27000000 0xFB0, 0x10000003 0xFB4, 0x42344241 0xFB8, 0x40334332 0xFBC, 0x43404150 0xFC0, 0x00004133 0xFC4, 0x44424444 0xFC8, 0x44415134 0xFCC, 0x51414251 0xFD0, 0x42414241 0xFD4, 0x50434252 0xFD8, 0x50444342 0xFDC, 0x42413444 0xFE0, 0x43514340 0xFE4, 0x44424444 0xFE8, 0x42514441 0xFEC, 0x40423443 0xFF0, 0x43424342 0xFF4, 0x43415042 0xFF8, 0x51415341 0xFFC, 0x54000D0D       数据: 0x00000005 0x00000000 0x00000000 0x00000000 0x00000000 0x00000000 0x00000000 0x00000000 0x00000000   ]   我还附上了验证失败过程中的详细 CCS 日志。   请问这是什么意思?我们该如何调试这个问题? QorIQ LS1设备 Re: Problem with DDRv tool on LS1088A 与新型DDR4 SO-DIMM相比,以前使用的是哪种SO-DIMM?新旧版本之间的任何变化 Re: Problem with DDRv tool on LS1088A 你好, 对于您提供的具体转储,最可行的解释是:控制器在训练期间引发了自动校准错误 ( ACE ),DDRv 的写入均衡搜索无法通过调整 WRLVL_START 找到有效的运行区域。首先,这指向 RESET/时钟/配置/DQ-map/SI 检查,其中 DDR RESET 和 DQn_MAP 排在首位,因为在 NXP 调试历史中,两者都反复与此 DDRv 故障类别相关联。因此,在调整裕量之前,请验证 DDR 时钟/RCW、DDR RESET 时序、SPD 衍生的秩/几何、DQ 映射和功耗/SI。 此致
記事全体を表示