2393034_ja-JP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2393034_ja-JP

2393034_ja-JP

#S32K312 IO入力設定

joshua9264_0-1783597102225.pngjoshua9264_0-1783597102225.png

LPUART0 RXを使用したいのですが、IMCR[699]を設定する必要がありますが、仕様にはIMCR[473]しかありません。どうすればよいでしょうか?


Re: #S32K312 IO input config

こんにちは、@joshua9264さん

S32K3xxリファレンスマニュアル改訂版12のセクション10.1.2には次のように記されています。

「添付のIOMUXファイルで定義されているIMCRは、SIUL2メモリマップセクションで定義されているIMCR番号に対して512のオフセットを持っています。」

オフセットの適用方法を明確にするために、RMのセクション4.4.3にも例が記載されています。


BR、VaneB

Re: #S32K312 IO input configはい、見つけました。ありがとう
Tags (1)
No ratings
Version history
Last update:
‎07-14-2026 03:31 AM
Updated by: