S32G399A-RDB3 QNX PFE Driver Problems Greetings, we try to get PFE running on a S32G399A-RDB3 board with QNX. As far as I can tell, this is a valid combination: BSP 37.0 PFE-FW_S32G_1.7.0 PFE-DRV-S32G_A53_QNX_1.4.0 It ends with a no carrier error on all network interfaces. Plugging the cable into different ethernet ports changes nothing. It used to work with gmac0. Any ideas? io pkt call: io-pkt-v6-hc -p tcpip -d pfe-2 pfe0_mac=000a0b0c0d66,pfe1_mac=001a1b1c1d66,pfe2_mac=002a2b2c2d66,class_fw=/proc/boot/s32g_pfe_class.fw,no_reset,mode0=sgmii,phy0=0,mode1=sgmii,phy1=1 Uboot parameters: Uboot is the same as from the Linux sdcard image with modified parmeters for qnx boot. setenv hwconfig "pcie0:mode=rc,clock=ext;pcie1:mode=sgmii,clock=ext,fmhz=125,xpcs_mode=2G5" setenv pfeng_mode 'enable,sgmii,sgmii,rgmii' setenv s32cc_gmac_mode disable setenv pfeng enable; s32ccgmac disable; s32ccgmac enable; setenv boot_qnx_atf 'mmc dev 0; fatload mmc 0:1 0x83e00000 s32g399a-rdb3.dtb; pfeng enable; s32ccgmac disable; s32ccgmac enable; fatload mmc 0:1 0x80080000 ifs-s32g399a-rdb.ui; bootm 0x80080000 - 0x83E00000' setenv bootcmd 'run boot_qnx_atf' saveenv Log: U-Boot 2020.04+g156b168010 (Jun 09 2023 - 10:14:25 +0000) CPU: NXP S32G399A rev. 1.1 Model: NXP S32G399A-RDB3 DRAM: 3.5 GiB MMC: FSL_SDHC: 0 Loading Environment from MMC... OK Configuring PCIe0 as RootComplex PCIe0: Failed to get link up PCI: Failed autoconfig bar 1c In: serial@401c8000 Out: serial@401c8000 Err: serial@401c8000 Board revision: RDB3 Revision F Net: EQOS phy: rgmii @ 1 Warning: eth_eqos (eth0) using random MAC address - 26:e4:e6:43:15:ad eth0: eth_eqosFailed to get speed of XPCS for emac1_xpcs PFE: emac0: sgmii emac1: sgmii emac2: rgmii , eth1: eth_pfeng Hit any key to stop autoboot: 3 2 1 0 switch to partitions #0, OK mmc0 is current device 50640 bytes read in 17 ms (2.8 MiB/s) 11948752 bytes read in 540 ms (21.1 MiB/s) ## Booting kernel from Legacy Image at 80080000 ... Image Name: Image Type: AArch64 Linux Kernel Image (uncompressed) Data Size: 11948688 Bytes = 11.4 MiB Load Address: 80080000 Entry Point: 80080000 Verifying Checksum ... OK ## Flattened Device Tree blob at 83e00000 Booting using the fdt blob at 0x83e00000 Loading Kernel Image Using Device Tree in place at 0000000083e00000, end 0000000083e0f5cf fixup: pfe0 set to 00:01:be:be:ef:11 fixup: pfe1 set to 00:01:be:be:ef:22 fixup: pfe1: update phy addr to 0x8 fixup: pfe2 set to 00:01:be:be:ef:33 Starting kernel ... Reserving RAM region for PFE driver on EVB/RDB Done. ClockCycles samples: 0 43600679 1 43600679 2 43600678 3 43600679 4 43600678 5 43600678 6 43600678 7 43600679 All ClockCycles offsets within tolerance Welcome to QNX Neutrino 7.1.0 on the NXP S32G399A RDB Board!! Starting watchdog... Starting serial driver ... Starting Networking driver (/dev/socket)... Process 4107 (ifconfig) exited status=0. Process 10 (sh) exited status=0. Process 9 (dhclient) exited status=0. cp: Can't open source file. (/proc/boot/libfci_cli) Process 20489 (cp) exited status=1. Starting SPI driver (/dev/spi0,1,2,3,4,5)... Starting I2C 0/1/2/3/4 driver (/dev/i2c0,1,2,3,4)... Starting USDHC0 memory card driver... [00] SIM="SDMMC" HBA="imx" [00,0,0] type=00 ver=05 resp=00 SDMMC: Process 24596 (chkqnx6fs) exited status=0. Process 28692 (mount) exited status=0. Starting QSPI Flash driver... Starting USB host driver (/dev/usb/*) Detected QSPI Flash: Macronix MX25UW512, JEDEC 0xC2 - 0x813A, Size: 0x4000000 Launching devb-umass for /dev/usb/* ... # Process 36891 (sleep) exited status=0. sh: /var/cetitec2/startup.sh: No such file or directory Process 45081 (sh) terminated signo=0 code=0 by process 0 value=0. slog2info Jan 01 00:00:00.023 random.4 low* 0 qcrypto: loading configuration file '/etc/qcrypto.conf' [qcrypto_common.c(190)] Jan 01 00:00:00.024 random.4..0 slog* 700 Random is using the Fortuna PRNG Jan 01 00:00:00.031 random.4 low 0 qcrypto: 'openssl' plugin loaded [qcrypto_plugins.c(354)] Jan 01 00:00:00.031 random.4..0 slog 700 Selecting timer as an entropy source Jan 01 00:00:00.032 random.4..0 slog 700 Registered path names Jan 01 00:00:00.032 random.4..0 slog 700 random: starting resmgr Jan 01 00:00:00.032 random.4..0 slog 700 random: Daemonizing the process Jan 01 00:00:00.042 devc_serlinflexd.7 slog* 0 serlinflexd_interrupt_attach: Attaching to interrupt 114 Jan 01 00:00:00.047 iopkt.8 main_buffer* 0 tcpip starting Jan 01 00:00:00.047 iopkt.8 main_buffer 0 smmu support is disabled Jan 01 00:00:00.049 iopkt.8 main_buffer 0 initializing IPsec... Jan 01 00:00:00.049 iopkt.8 main_buffer 0 done Jan 01 00:00:00.049 iopkt.8 main_buffer 0 IPsec: Initialized Security Association Processing. Jan 01 00:00:00.051 iopkt.8 main_buffer 0 devnp-pfe-2.so pfe0_mac=000a0b0c0d66,pfe1_mac=001a1b1c1d66,pfe2_mac=002a2b2c2d66,class_fw=/proc/boot/s32g_pfe_class.fw,pfe0_mode=sgmii,pfe0_phy=0,pfe1_mode=sgmii,pfe1_phy=1 Jan 01 00:00:00.052 io_pkt_v6_hc.8 slog* 0 INF[src/pfe_drv.c:1377]: VERSION INFO Driver version: 1.4.0 Driver commit hash: 2f3265a49ac18f94ba5e48254c8f870fe7bfc511 PFE_CFG_MULTI_INSTANCE_SUPPORT: 0 PFE_CFG_LOCAL_IF: 6 PFE_CFG_MASTER_IF: 6 PFE_CFG_SC_HIF: 1 PFE_CFG_HIF_RING_LENGTH: 256 PFE_CFG_PFE0_PROMISC: 1 PFE_CFG_PFE1_PROMISC: 1 PFE_CFG_PFE2_PROMISC: 1 Jan 01 00:00:00.052 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1384]: --- Safe IRQ enabled. No InterrupAttach() or InterruptAttach_r() allowed. Jan 01 00:00:00.052 io_pkt_v6_hc.8 slog 0 INF[src/pfe_fw.c:83]: 42792 bytes read Jan 01 00:00:00.053 io_pkt_v6_hc.8 slog 0 INF[src/pfe_fw.c:89]: Loaded firmware file: /proc/boot/s32g_pfe_class.fw Jan 01 00:00:00.053 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1477]: MII mode configuration for pfe0/EMAC0 not found. Using SGMII. Jan 01 00:00:00.053 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1477]: MII mode configuration for pfe1/EMAC1 not found. Using SGMII. Jan 01 00:00:00.053 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1477]: MII mode configuration for pfe2/EMAC2 not found. Using RGMII. Jan 01 00:00:00.053 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1495]: Issuing PFE peripheral reset... Jan 01 00:00:00.274 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1496]: PFE reset OK. Jan 01 00:00:00.274 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:3519]: PFE CBUS p0x46000000 mapped @ v0x38f2e23000 Jan 01 00:00:00.274 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:3524]: HW version 0x101 Jan 01 00:00:00.274 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hw_feature.c:95]: Silicon S32G3 Jan 01 00:00:00.274 io_pkt_v6_hc.8 slog 0 WRN[hw/s32g/pfe_platform_master.c:3536]: Fail-Stop mode disabled Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2687]: PFE_ERRORS:Parity instance created Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2702]: PFE_ERRORS:Watchdog instance created Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2718]: PFE_ERRORS:Bus Error instance created Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2731]: PFE_ERRORS:FW Fail Stop instance created Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2744]: PFE_ERRORS:Host Fail Stop instance created Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2757]: PFE_ERRORS:Fail Stop instance created Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2770]: PFE_ERRORS:ECC Err instance created Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:1766]: BMU1 buffer base: p0xc0000000 Jan 01 00:00:00.277 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:1810]: BMU2 buffer base: p0x83000000 (0x200000 bytes) Jan 01 00:00:00.279 io_pkt_v6_hc.8 slog 0 INF[src/oal_irq_qnx.c:117]: PFE BMU IRQ Worker started (IRQ ID: 226) Jan 01 00:00:00.279 io_pkt_v6_hc.8 slog 0 WRN[hw/s32g/pfe_platform_master.c:2194]: The option 'g2_ordered_class_writes' is disabled. Jan 01 00:00:00.279 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_bmu_csr.c:96]: BMU_EMPTY_INT (BMU @ p0x88000). Pool ready. Jan 01 00:00:00.279 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_bmu_csr.c:96]: BMU_EMPTY_INT (BMU @ p0x8c000). Pool ready. Jan 01 00:00:00.281 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2239]: Firmware .elf detected Jan 01 00:00:00.281 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2248]: Uploading CLASS firmware Jan 01 00:00:00.281 io_pkt_v6_hc.8 slog 0 INF[src/pfe_pe.c:609]: Selected FW loading OPs to load 8 PEs in parallel Jan 01 00:00:00.285 io_pkt_v6_hc.8 slog 0 INF[src/pfe_pe.c:1945]: pfe_ct.h file version"92367c0e25f21f49217a9b08168ad2c8" Jan 01 00:00:00.288 io_pkt_v6_hc.8 slog 0 INF[src/pfe_pe.c:2422]: [FW VERSION] 1.7.0, Build: Jun 2 2023, 13:48:57 (nogitaaa), ID: 0x31454650 Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 WRN[hw/s32g/pfe_platform_master.c:2312]: VLAN ID incorrect or not set. Using default VLAN ID = 0x01. Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 WRN[hw/s32g/pfe_platform_master.c:2318]: VLAN stats size incorrect or not set. Using default VLAN stats size = 20. Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 INF[src/pfe_l2br.c:1181]: Software vlan hash table @ p0x20001228 Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 INF[src/pfe_l2br.c:1286]: Fall-back bridge domain @ 0x20000a7c (class) Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 INF[src/pfe_l2br.c:1287]: Default bridge domain @ 0x20000a74 (class) Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2412]: Routing table created, Hash Table @ p0x80014000, Pool @ p0x8001c000 (65536 bytes) Jan 01 00:00:00.407 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_chnl.c:1997]: Initializing RX buffer pool. Depth: 256; Buffer Size: 2048; Cache Line Size: 64 Jan 01 00:00:00.408 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_chnl.c:1997]: Initializing RX buffer pool. Depth: 256; Buffer Size: 2048; Cache Line Size: 64 Jan 01 00:00:00.409 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_chnl.c:1997]: Initializing RX buffer pool. Depth: 256; Buffer Size: 2048; Cache Line Size: 64 Jan 01 00:00:00.508 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:3705]: Feature err051211_workaround: DISABLED Jan 01 00:00:00.509 iopkt.8 main_buffer 0 pfe0 Jan 01 00:00:00.509 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2152]: pfe0: Using PHY mode: MDIO=0, ADDR=0, CLAUSE=0, RESET=0 Jan 01 00:00:00.509 io_pkt_v6_hc.8 slog 0 INF[src/oal_irq_qnx.c:117]: PFE HIF0 IRQ Worker started (IRQ ID: 222) Jan 01 00:00:00.509 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1795]: Adding 00:0a:0b:0c:0d:66 to pfe0 Jan 01 00:00:00.511 iopkt.8 main_buffer 0 pfe1 Jan 01 00:00:00.511 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2298]: Speed/duplex configuration for pfe0 not found. Using 1 Gbps/full-duplex. Jan 01 00:00:00.511 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:336]: Attempt to register HIF client: 0 Jan 01 00:00:00.511 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:1189]: HIF driver started Jan 01 00:00:00.511 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2363]: New PFE device: 0, ID: 0 Jan 01 00:00:00.511 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2152]: pfe1: Using PHY mode: MDIO=1, ADDR=0, CLAUSE=0, RESET=0 Jan 01 00:00:00.511 io_pkt_v6_hc.8 slog 0 INF[src/oal_irq_qnx.c:117]: PFE HIF1 IRQ Worker started (IRQ ID: 223) Jan 01 00:00:00.511 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1795]: Adding 00:1a:1b:1c:1d:66 to pfe1 Jan 01 00:00:00.513 iopkt.8 main_buffer 0 pfe2 Jan 01 00:00:00.513 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2298]: Speed/duplex configuration for pfe1 not found. Using 1 Gbps/full-duplex. Jan 01 00:00:00.513 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:336]: Attempt to register HIF client: 1 Jan 01 00:00:00.513 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:1189]: HIF driver started Jan 01 00:00:00.513 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2363]: New PFE device: 1, ID: 2 Jan 01 00:00:00.513 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2145]: pfe2: Using static PHY mode, RESET=0 Jan 01 00:00:00.513 io_pkt_v6_hc.8 slog 0 INF[src/oal_irq_qnx.c:117]: PFE HIF2 IRQ Worker started (IRQ ID: 224) Jan 01 00:00:00.513 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1795]: Adding 00:2a:2b:2c:2d:66 to pfe2 Jan 01 00:00:00.515 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2298]: Speed/duplex configuration for pfe2 not found. Using 1 Gbps/full-duplex. Jan 01 00:00:00.515 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:336]: Attempt to register HIF client: 2 Jan 01 00:00:00.515 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:1189]: HIF driver started Jan 01 00:00:00.515 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2363]: New PFE device: 2, ID: 4 Jan 01 00:00:00.530 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2702]: Adding 00:0a:0b:0c:0d:66 to pfe0 Jan 01 00:00:00.530 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2707]: Unable to assign MAC address 00:0a:0b:0c:0d:66 to the pfe0 Jan 01 00:00:00.530 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode Jan 01 00:00:00.538 io_pkt_v6_hc.8 slog 0 INF[src/pfe_mdio.c:427]: pfe0: PHY @ bus 0 addr 0 not found. Switching to static mode. Jan 01 00:00:00.538 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2829]: EMAC speed change for SGMII is currently not supported. Jan 01 00:00:00.538 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0 Jan 01 00:00:00.540 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode Jan 01 00:00:00.540 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0 Jan 01 00:00:00.542 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0 Jan 01 00:00:00.542 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17 Jan 01 00:00:00.542 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode Jan 01 00:00:00.542 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0 Jan 01 00:00:00.542 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:00:00:00:01 into emac0: 17 Jan 01 00:00:00.542 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0 Jan 01 00:00:00.542 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17 Jan 01 00:00:00.542 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode Jan 01 00:00:00.542 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2829]: EMAC speed change for SGMII is currently not supported. Jan 01 00:00:00.542 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 01:00:5e:00:00:01 to emac0 Jan 01 00:00:00.544 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0 Jan 01 00:00:00.544 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:00:00:00:01 into emac0: 17 Jan 01 00:00:00.544 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0 Jan 01 00:00:00.544 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17 Jan 01 00:00:00.544 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode Jan 01 00:00:00.554 spi_master.24585 normal* 0 Starting spi-master resource manager Jan 01 00:00:00.558 spi_master.24587 normal* 0 Starting spi-master resource manager Jan 01 00:00:00.561 spi_master.24588 normal* 0 Starting spi-master resource manager Jan 01 00:00:00.565 spi_master.24589 normal* 0 Starting spi-master resource manager Jan 01 00:00:00.582 devb_sdmmc_mx8x.24595 slog* 1800 devb-sdmmc-mx8x 1.00A (Jun 23 2026 09:45:48) Jan 01 00:00:00.583 devb_sdmmc_mx8x.24595 slog 0 libcam.so (Jun 22 2020 21:33:15) bver 7010003 Jan 01 00:00:00.594 devb_sdmmc_mx8x.24595 slog 1800 sdio_cd: insertion path 0, cd state 0x1 Jan 01 00:00:00.644 devb_sdmmc_mx8x.24595 slog 1800 SD CID: Jan 01 00:00:00.644 devb_sdmmc_mx8x.24595 slog 1800 MID 0x27, OID 0x5048, PNM SD32G Jan 01 00:00:00.644 devb_sdmmc_mx8x.24595 slog 1800 PRV 0x62, PSN 0x6c62d132, MDT 4-2023 Jan 01 00:00:00.644 devb_sdmmc_mx8x.24595 slog 1800 SD CSD: Jan 01 00:00:00.644 devb_sdmmc_mx8x.24595 slog 1800 CSD_STRUCTURE 1, SPEC_VERS 0, CCC 0x5b5 Jan 01 00:00:00.644 devb_sdmmc_mx8x.24595 slog 1800 TAAC 14, NSAC 0, TRAN_SPEED 50 Jan 01 00:00:00.644 devb_sdmmc_mx8x.24595 slog 1800 C_SIZE 59023, C_SIZE_MULT 0 Jan 01 00:00:00.644 devb_sdmmc_mx8x.24595 slog 1800 READ_BL_LEN 9, WRITE_BL_LEN 9 Jan 01 00:00:00.644 devb_sdmmc_mx8x.24595 slog 1800 ERASE GRP_SIZE 0, GRP_MULT 0, SIZE 127 Jan 01 00:00:00.644 devb_sdmmc_mx8x.24595 slog 1800 blksz 512, sectors 60440576, dtr 25000000 Jan 01 00:00:00.644 devb_sdmmc_mx8x.24595 slog 1800 SD SW CAPS: Jan 01 00:00:00.644 devb_sdmmc_mx8x.24595 slog 1800 bus mode 0x3, cmd sys 0x1 Jan 01 00:00:00.644 devb_sdmmc_mx8x.24595 slog 1800 drv type 0x1, curr limit 0x1 Jan 01 00:00:00.644 devb_sdmmc_mx8x.24595 slog 1800 dtr 50000000 Jan 01 00:00:00.644 devb_sdmmc_mx8x.24595 slog 1800 CFG: Timing HS, DTR 50000000, Bus Width 4 bit Jan 01 00:00:00.645 devb_sdmmc_mx8x.24595 slog 100 cam-disk.so (Jun 22 2020 21:33:17) Jan 01 00:00:00.647 devb_sdmmc_mx8x.24595 slog 0 scsi_interpret_sense (sdmmc ptl-0:0:0): cam_status=c4, scsi_status=2, flag=00000040, vuflag=0008, cmd=1a, error=70, sense=5, asc=24, ascq=0 Jan 01 00:00:00.647 devb_sdmmc_mx8x.24595 slog 0 scsi_interpret_sense (sdmmc ptl-0:0:0): cam_status=c4, scsi_status=2, flag=00000040, vuflag=0008, cmd=5a, error=70, sense=5, asc=24, ascq=0 Jan 01 00:00:00.647 devb_sdmmc_mx8x.24595 slog 0 scsi_interpret_sense (sdmmc ptl-0:0:0): cam_status=c4, scsi_status=2, flag=00000040, vuflag=0008, cmd=5a, error=70, sense=5, asc=24, ascq=0 Jan 01 00:00:01.827 devb_sdmmc_mx8x.24595 slog 1000 fs-qnx6: Allocation strategy 0 Jan 01 00:00:01.827 devb_sdmmc_mx8x.24595 slog 1000 fs-qnx6: Use btree directory 0 Jan 01 00:00:01.828 devb_sdmmc_mx8x.24595 slog 1000 fs-qnx6: fs-qnx6: trim (0,1048576,2) was not requested, and is NOT supported Jan 01 00:00:01.833 io_usb_otg.36885 slog* 0 main(453)[tid:1]: io-usb-otg (Jun 13 2020 20:10:17) args: -d hcd-ehci-mx28 ioport=0x44064100,irq=243,ulpi,no_stream,verbose=5 Jan 01 00:00:01.835 devf_qspi_s32g.36884 slog* 0 (devf t1::f3s_qspi_ident:73) Page size: 256 Jan 01 00:00:01.835 devf_qspi_s32g.36884 slog 0 (devf t1::f3s_qspi_ident:74) Total chip size: 0x4000000, Unit size: 0x10000 Jan 01 00:00:01.839 io_usb_otg.36885 slog 0 ehci_init: Initialiaing with sever version: 2 Jan 01 00:00:01.839 io_usb_otg.36885 slog 0 ehci_controller_init(4303): devu-hcd-ehci-mx28.so (Apr 19 2024 13:44:54): args ulpi,no_stream,verbose=5 Jan 01 00:00:01.840 io_usb_otg.36885 slog 8 usb_enum_port(94)[tid:1]: busno 0, parent -1, port 0, High speed Jan 01 00:00:01.840 io_usb_otg.36885 slog 11 usb_client_descriptor_get(198)[tid:1]: (type 1, index 0, length 😎 Jan 01 00:00:01.840 io_usb_otg.36885 slog 12 usb_device_set_address(245)[tid:1]: b:0 devno 0 Jan 01 00:00:01.840 io_usb_otg.36885 slog 11 usb_client_descriptor_get(198)[tid:1]: (type 1, index 0, length 18) Jan 01 00:00:01.841 io_usb_otg.36885 slog 11 usb_client_descriptor_get(198)[tid:1]: (type 2, index 0, length 9) Jan 01 00:00:01.841 io_usb_otg.36885 slog 11 usb_client_descriptor_get(198)[tid:1]: (type 2, index 0, length 25) Jan 01 00:00:01.841 io_usb_otg.36885 slog 8 usb_enum_port(141)[tid:1]: vid 0x0000, did 0x0000 enumerated(busno 0, devno 0:0) Jan 01 00:00:01.841 io_usb_otg.36885 slog 11 hub_state_inserted(569)[tid:1]: bdentry 0, dentry 0 0 Jan 01 00:00:01.841 io_usb_otg.36885 slog 13 hub_configuration_enable(263)[tid:1]: 1 Jan 01 00:00:01.943 io_usb_otg.36885 slog 0 usbh_timeout_init(203)[tid:1]: Complete Jan 01 00:00:01.954 io_usb_otg.36885 slog 0 read_vid_pid: ULPI VID 0x0424 PID 0x0009 Jan 01 00:00:01.954 io_usb_otg.36885 slog 0 s32g_phy_set_vbus: set_vbus off Jan 01 00:00:01.968 io_usb_otg.36885 slog 0 s32g_phy_set_vbus: set_vbus on Jan 01 00:00:01.979 io_usb_otg.36885 slog 0 ehci_get_port_status(3568 0x44064100): port=0, tpstatus 10100 e_pstatus 8c001000 Jan 01 00:00:01.979 io_usb_otg.36885 slog 8 usb_enum_port_extract(172)[tid:7]: (busno 0, pdevno 0, portno 1) Jan 01 00:00:01.979 io_usb_otg.36885 slog 8 usb_enum_port_extract(192)[tid:7]: status (2) Jan 01 00:00:01.983 devb_umass.36886 slog* 900 devb-umass 1.00A (Jun 22 2020 21:33:41) Jan 01 00:00:01.984 devb_umass.36886 slog 0 libcam.so (Jun 22 2020 21:33:15) bver 7010003 Jan 01 00:00:01.985 io_usb_otg.36885 slog 0 usbdi_client_connect(58)[tid:5]: pid 36886 proc=proc/boot/devb-umass usbdi_client 32eebb9a80 Jan 01 00:00:01.986 io_usb_otg.36885 slog 0 usbdi_resmgr_connect(310)[tid:5]: usbdi_resmgr_connect: pid 36886 usbdi_client 32eebb9a80 Jan 01 00:00:01.986 devb_umass.36886 slog 0 usbdi debug path /pps/usb/debug/ doesn't exist Process 49177 (slog2info) exited status=0. # ifconfig lo0: flags=8049 mtu 33136 inet 127.0.0.1 netmask 0xff000000 inet6 ::1 prefixlen 128 inet6 fe80::1%lo0 prefixlen 64 scopeid 0x1 pfe0: flags=8843 mtu 1500 capabilities=1f enabled=0 address: 00:0a:0b:0c:0d:66 media: Ethernet none (1000baseT full-duplex) status: active inet 0.0.0.0 netmask 0xff000000 broadcast 255.255.255.255 inet6 fe80::20a:bff:fe0c:d66%pfe0 prefixlen 64 scopeid 0x11 pfe1: flags=8802 mtu 1500 capabilities=1f enabled=0 address: 00:1a:1b:1c:1d:66 media: Ethernet none (1000baseT full-duplex) status: no carrier pfe2: flags=8802 mtu 1500 capabilities=1f enabled=0 address: 00:2a:2b:2c:2d:66 media: Ethernet none (1000baseT full-duplex) status: no carrier Process 57369 (ifconfig) exited status=0. # Re: S32G399A-RDB3 QNX PFE Driver Problems Ok, so I replaced s32g_pfe_class.fw and s32g_pfe_util.fw with the files from PFE-FW_S32G_1.6.0.zip here: https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=14074877 Uboot parameters: setenv boot_qnx_atf 'mmc dev 0; fatload mmc 0:1 0x83e00000 s32g399a-rdb3.dtb; run atf_fdt_0to3; run atf_fdt_4to7; fatload mmc 0:1 0x80080000 ifs-s32g399a-rdb.ui; pfeng enable; s32ccgmac disable; s32ccgmac enable; bootm 0x80080000 - 0x83E00000' setenv atf_fdt_0to3 'fdt addr 0x83e00000; fdt resize; fdt set /cpus/cpu@1 cpu-release-addr <0x0 0xa0000010>; fdt set /cpus/cpu@100 cpu-release-addr <0x0 0xa0000010>; fdt set /cpus/cpu@101 cpu-release-addr <0x0 0xa0000010>;' setenv atf_fdt_4to7 'fdt set /cpus/cpu@2 cpu-release-addr <0x0 0xa0000010>; fdt set /cpus/cpu@3 cpu-release-addr <0x0 0xa0000010>; fdt set /cpus/cpu@102 cpu-release-addr <0x0 0xa0000010>; fdt set /cpus/cpu@103 cpu-release-addr <0x0 0xa0000010>;' setenv release_cpus 'run cpu_trap; mp 1 release 0xa0000000; mp 2 release 0xa0000000; mp 3 release 0xa0000000; mp 4 release 0xa0000000; mp 5 release 0xa0000000; mp 6 release 0xa0000000; mp 7 release 0xa0000000;' setenv cpu_trap 'dcache off; mw.l 0xa0000000 0xd503205f; mw.l 0xa0000004 0x58000060; mw.l 0xa0000008 0xb4ffffc0; mw.l 0xa000000C 0xd61f0000; mw.q 0xa0000010 0x00000000; dcache on;' setenv bootcmd 'run boot_qnx_atf' setenv hwconfig "pcie0:mode=rc,clock=ext;pcie1:mode=sgmii,clock=ext,fmhz=125,xpcs_mode=2G5" setenv pfeng_mode 'enable,sgmii,sgmii,rgmii' setenv s32cc_gmac_mode disable saveenv Note: I removed the release_cpus command from boot_qnx_atf because then I would havef a cpu 1 error. Doesn't look much better to me: NOTICE: BL2: v2.5(release):bsp37.0_rc6-2.5 NOTICE: BL2: Built : 09:12:21, Jun 13 2023 NOTICE: BL2: Booting BL31 U-Boot 2020.04+g156b168010 (Jun 09 2023 - 10:14:25 +0000) CPU: NXP S32G399A rev. 1.1 Model: NXP S32G399A-RDB3 DRAM: 3.5 GiB MMC: FSL_SDHC: 0 Loading Environment from MMC... OK Configuring PCIe0 as RootComplex PCIe0: Failed to get link up PCI: Failed autoconfig bar 1c In: serial@401c8000 Out: serial@401c8000 Err: serial@401c8000 Board revision: RDB3 Revision F Net: EQOS phy: rgmii @ 1 Warning: eth_eqos (eth0) using random MAC address - 16:ec:a0:4e:1d:7c eth0: eth_eqosFailed to get speed of XPCS for emac1_xpcs PFE: emac0: sgmii emac1: sgmii emac2: rgmii , eth1: eth_pfeng Hit any key to stop autoboot: 3 2 1 0 switch to partitions #0, OK mmc0 is current device 50640 bytes read in 17 ms (2.8 MiB/s) 11950600 bytes read in 534 ms (21.3 MiB/s) ## Booting kernel from Legacy Image at 80080000 ... Image Name: Image Type: AArch64 Linux Kernel Image (uncompressed) Data Size: 11950536 Bytes = 11.4 MiB Load Address: 80080000 Entry Point: 80080000 Verifying Checksum ... OK ## Flattened Device Tree blob at 83e00000 Booting using the fdt blob at 0x83e00000 Loading Kernel Image Using Device Tree in place at 0000000083e00000, end 0000000083e0ffff fixup: pfe0 set to 00:01:be:be:ef:11 fixup: pfe1 set to 00:01:be:be:ef:22 fixup: pfe1: update phy addr to 0x8 fixup: pfe2 set to 00:01:be:be:ef:33 Starting kernel ... Reserving RAM region for PFE driver on EVB/RDB Done. ClockCycles samples: 0 43642864 1 43642864 2 43642864 3 43642864 4 43642864 5 43642864 6 43642864 7 43642864 All ClockCycles offsets within tolerance Welcome to QNX Neutrino 7.1.0 on the NXP S32G399A RDB Board!! Starting watchdog... Starting serial driver ... Starting Networking driver (/dev/socket)... Process 4107 (ifconfig) exited status=0. Process 10 (sh) exited status=0. Process 9 (dhclient) exited status=0. cp: Can't open source file. (/proc/boot/libfci_cli) Process 20489 (cp) exited status=1. Starting SPI driver (/dev/spi0,1,2,3,4,5)... Starting I2C 0/1/2/3/4 driver (/dev/i2c0,1,2,3,4)... Starting USDHC0 memory card driver... [00] SIM="SDMMC" HBA="imx" [00,0,0] type=00 ver=05 resp=00 SDMMC: Process 24596 (chkqnx6fs) exited status=0. Process 28692 (mount) exited status=0. Starting QSPI Flash driver... Starting USB host driver (/dev/usb/*) Detected QSPI Flash: Macronix MX25UW512, JEDEC 0xC2 - 0x813A, Size: 0x4000000 Launching devb-umass for /dev/usb/* ... # ifconfig lo0: flags=8049 mtu 33136 inet 127.0.0.1 netmask 0xff000000 inet6 ::1 prefixlen 128 inet6 fe80::1%lo0 prefixlen 64 scopeid 0x1 pfe0: flags=8843 mtu 1500 capabilities=1f enabled=0 address: 00:0a:0b:0c:0d:66 media: Ethernet none (1000baseT full-duplex) status: active inet 0.0.0.0 netmask 0xff000000 broadcast 255.255.255.255 inet6 fe80::20a:bff:fe0c:d66%pfe0 prefixlen 64 scopeid 0x11 pfe1: flags=8802 mtu 1500 capabilities=1f enabled=0 address: 00:1a:1b:1c:1d:66 media: Ethernet none (1000baseT full-duplex) status: no carrier pfe2: flags=8802 mtu 1500 capabilities=1f enabled=0 address: 00:2a:2b:2c:2d:66 media: Ethernet none (1000baseT full-duplex) status: no carrier Process 40985 (ifconfig) exited status=0. # Process 36891 (sleep) exited status=0. sh: /var/cetitec2/startup.sh: No such file or directory Process 53273 (sh) terminated signo=0 code=0 by process 0 value=0. # ifconfig lo0: flags=8049 mtu 33136 inet 127.0.0.1 netmask 0xff000000 inet6 ::1 prefixlen 128 inet6 fe80::1%lo0 prefixlen 64 scopeid 0x1 pfe0: flags=8843 mtu 1500 capabilities=1f enabled=0 address: 00:0a:0b:0c:0d:66 media: Ethernet none (1000baseT full-duplex) status: active inet 0.0.0.0 netmask 0xff000000 broadcast 255.255.255.255 inet6 fe80::20a:bff:fe0c:d66%pfe0 prefixlen 64 scopeid 0x11 pfe1: flags=8802 mtu 1500 capabilities=1f enabled=0 address: 00:1a:1b:1c:1d:66 media: Ethernet none (1000baseT full-duplex) status: no carrier pfe2: flags=8802 mtu 1500 capabilities=1f enabled=0 address: 00:2a:2b:2c:2d:66 media: Ethernet none (1000baseT full-duplex) status: no carrier # slog2info | grep pfe Jan 01 00:00:00.051 iopkt.8 main_buffer 0 devnp-pfe-2.so pfe0_mac=000a0b0c0d66,pfe1_mac=001a1b1c1d66,pfe2_mac=002a2b2c2d66,class_fw=/proc/boot/s32g_pfe_class.fw Jan 01 00:00:00.052 io_pkt_v6_hc.8 slog* 0 INF[src/pfe_drv.c:1377]: VERSION INFO Jan 01 00:00:00.052 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1384]: --- Safe IRQ enabled. No InterrupAttach() or InterruptAttach_r() allowed. Jan 01 00:00:00.052 io_pkt_v6_hc.8 slog 0 INF[src/pfe_fw.c:83]: 49480 bytes read Jan 01 00:00:00.052 io_pkt_v6_hc.8 slog 0 INF[src/pfe_fw.c:89]: Loaded firmware file: /proc/boot/s32g_pfe_class.fw Jan 01 00:00:00.053 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1477]: MII mode configuration for pfe0/EMAC0 not found. Using SGMII. Jan 01 00:00:00.053 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1477]: MII mode configuration for pfe1/EMAC1 not found. Using SGMII. Jan 01 00:00:00.053 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1477]: MII mode configuration for pfe2/EMAC2 not found. Using RGMII. Jan 01 00:00:00.053 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1495]: Issuing PFE peripheral reset... Jan 01 00:00:00.274 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1496]: PFE reset OK. Jan 01 00:00:00.274 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:3519]: PFE CBUS p0x46000000 mapped @ v0x1abef95000 Jan 01 00:00:00.274 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:3524]: HW version 0x101 Jan 01 00:00:00.274 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hw_feature.c:95]: Silicon S32G3 Jan 01 00:00:00.274 io_pkt_v6_hc.8 slog 0 WRN[hw/s32g/pfe_platform_master.c:3536]: Fail-Stop mode disabled Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2687]: PFE_ERRORS:Parity instance created Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2702]: PFE_ERRORS:Watchdog instance created Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2718]: PFE_ERRORS:Bus Error instance created Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2731]: PFE_ERRORS:FW Fail Stop instance created Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2744]: PFE_ERRORS:Host Fail Stop instance created Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2757]: PFE_ERRORS:Fail Stop instance created Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2770]: PFE_ERRORS:ECC Err instance created Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:1766]: BMU1 buffer base: p0xc0000000 Jan 01 00:00:00.277 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:1810]: BMU2 buffer base: p0x83000000 (0x200000 bytes) Jan 01 00:00:00.279 io_pkt_v6_hc.8 slog 0 WRN[hw/s32g/pfe_platform_master.c:2194]: The option 'g2_ordered_class_writes' is disabled. Jan 01 00:00:00.279 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_bmu_csr.c:96]: BMU_EMPTY_INT (BMU @ p0x88000). Pool ready. Jan 01 00:00:00.279 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_bmu_csr.c:96]: BMU_EMPTY_INT (BMU @ p0x8c000). Pool ready. Jan 01 00:00:00.281 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2239]: Firmware .elf detected Jan 01 00:00:00.281 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2248]: Uploading CLASS firmware Jan 01 00:00:00.281 io_pkt_v6_hc.8 slog 0 INF[src/pfe_pe.c:609]: Selected FW loading OPs to load 8 PEs in parallel Jan 01 00:00:00.285 io_pkt_v6_hc.8 slog 0 INF[src/pfe_pe.c:1945]: pfe_ct.h file version"92367c0e25f21f49217a9b08168ad2c8" Jan 01 00:00:00.288 io_pkt_v6_hc.8 slog 0 INF[src/pfe_pe.c:2422]: [FW VERSION] 1.6.0, Build: Mar 15 2023, 12:37:54 (), ID: 0x31454650 Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 WRN[hw/s32g/pfe_platform_master.c:2312]: VLAN ID incorrect or not set. Using default VLAN ID = 0x01. Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 WRN[hw/s32g/pfe_platform_master.c:2318]: VLAN stats size incorrect or not set. Using default VLAN stats size = 20. Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 INF[src/pfe_l2br.c:1181]: Software vlan hash table @ p0x20001208 Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 INF[src/pfe_l2br.c:1286]: Fall-back bridge domain @ 0x20000a44 (class) Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 INF[src/pfe_l2br.c:1287]: Default bridge domain @ 0x20000a3c (class) Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2412]: Routing table created, Hash Table @ p0x80014000, Pool @ p0x8001c000 (65536 bytes) Jan 01 00:00:00.407 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_chnl.c:1997]: Initializing RX buffer pool. Depth: 256; Buffer Size: 2048; Cache Line Size: 64 Jan 01 00:00:00.408 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_chnl.c:1997]: Initializing RX buffer pool. Depth: 256; Buffer Size: 2048; Cache Line Size: 64 Jan 01 00:00:00.409 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_chnl.c:1997]: Initializing RX buffer pool. Depth: 256; Buffer Size: 2048; Cache Line Size: 64 Jan 01 00:00:00.508 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:3705]: Feature err051211_workaround: DISABLED Jan 01 00:00:00.509 iopkt.8 main_buffer 0 pfe0 Jan 01 00:00:00.509 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2145]: pfe0: Using static PHY mode, RESET=0 Jan 01 00:00:00.510 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1795]: Adding 00:0a:0b:0c:0d:66 to pfe0 Jan 01 00:00:00.512 iopkt.8 main_buffer 0 pfe1 Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2298]: Speed/duplex configuration for pfe0 not found. Using 1 Gbps/full-duplex. Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:336]: Attempt to register HIF client: 0 Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:1189]: HIF driver started Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2363]: New PFE device: 0, ID: 0 Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2145]: pfe1: Using static PHY mode, RESET=0 Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1795]: Adding 00:1a:1b:1c:1d:66 to pfe1 Jan 01 00:00:00.514 iopkt.8 main_buffer 0 pfe2 Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2298]: Speed/duplex configuration for pfe1 not found. Using 1 Gbps/full-duplex. Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:336]: Attempt to register HIF client: 1 Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:1189]: HIF driver started Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2363]: New PFE device: 1, ID: 2 Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2145]: pfe2: Using static PHY mode, RESET=0 Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1795]: Adding 00:2a:2b:2c:2d:66 to pfe2 Jan 01 00:00:00.516 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2298]: Speed/duplex configuration for pfe2 not found. Using 1 Gbps/full-duplex. Jan 01 00:00:00.516 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:336]: Attempt to register HIF client: 2 Jan 01 00:00:00.516 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:1189]: HIF driver started Jan 01 00:00:00.516 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2363]: New PFE device: 2, ID: 4 Jan 01 00:00:00.531 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2702]: Adding 00:0a:0b:0c:0d:66 to pfe0 Jan 01 00:00:00.531 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2707]: Unable to assign MAC address 00:0a:0b:0c:0d:66 to the pfe0 Jan 01 00:00:00.531 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode Jan 01 00:00:00.531 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2829]: EMAC speed change for SGMII is currently not supported. Jan 01 00:00:00.532 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0 Jan 01 00:00:00.534 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode Jan 01 00:00:00.534 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0 Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0 Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17 Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0 Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:00:00:00:01 into emac0: 17 Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0 Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17 Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2829]: EMAC speed change for SGMII is currently not supported. Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 01:00:5e:00:00:01 to emac0 Jan 01 00:00:00.538 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0 Jan 01 00:00:00.538 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:00:00:00:01 into emac0: 17 Jan 01 00:00:00.538 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0 Jan 01 00:00:00.538 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17 Jan 01 00:00:00.538 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode # slog2info | grep io_pkt_v6_hc Jan 01 00:00:00.052 io_pkt_v6_hc.8 slog* 0 INF[src/pfe_drv.c:1377]: VERSION INFO Jan 01 00:00:00.052 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1384]: --- Safe IRQ enabled. No InterrupAttach() or InterruptAttach_r() allowed. Jan 01 00:00:00.052 io_pkt_v6_hc.8 slog 0 INF[src/pfe_fw.c:83]: 49480 bytes read Jan 01 00:00:00.052 io_pkt_v6_hc.8 slog 0 INF[src/pfe_fw.c:89]: Loaded firmware file: /proc/boot/s32g_pfe_class.fw Jan 01 00:00:00.053 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1477]: MII mode configuration for pfe0/EMAC0 not found. Using SGMII. Jan 01 00:00:00.053 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1477]: MII mode configuration for pfe1/EMAC1 not found. Using SGMII. Jan 01 00:00:00.053 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1477]: MII mode configuration for pfe2/EMAC2 not found. Using RGMII. Jan 01 00:00:00.053 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1495]: Issuing PFE peripheral reset... Jan 01 00:00:00.274 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1496]: PFE reset OK. Jan 01 00:00:00.274 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:3519]: PFE CBUS p0x46000000 mapped @ v0x1abef95000 Jan 01 00:00:00.274 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:3524]: HW version 0x101 Jan 01 00:00:00.274 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hw_feature.c:95]: Silicon S32G3 Jan 01 00:00:00.274 io_pkt_v6_hc.8 slog 0 WRN[hw/s32g/pfe_platform_master.c:3536]: Fail-Stop mode disabled Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2687]: PFE_ERRORS:Parity instance created Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2702]: PFE_ERRORS:Watchdog instance created Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2718]: PFE_ERRORS:Bus Error instance created Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2731]: PFE_ERRORS:FW Fail Stop instance created Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2744]: PFE_ERRORS:Host Fail Stop instance created Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2757]: PFE_ERRORS:Fail Stop instance created Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2770]: PFE_ERRORS:ECC Err instance created Jan 01 00:00:00.275 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:1766]: BMU1 buffer base: p0xc0000000 Jan 01 00:00:00.277 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:1810]: BMU2 buffer base: p0x83000000 (0x200000 bytes) Jan 01 00:00:00.279 io_pkt_v6_hc.8 slog 0 WRN[hw/s32g/pfe_platform_master.c:2194]: The option 'g2_ordered_class_writes' is disabled. Jan 01 00:00:00.279 io_pkt_v6_hc.8 slog 0 INF[src/oal_irq_qnx.c:117]: PFE BMU IRQ Worker started (IRQ ID: 226) Jan 01 00:00:00.279 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_bmu_csr.c:96]: BMU_EMPTY_INT (BMU @ p0x88000). Pool ready. Jan 01 00:00:00.279 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_bmu_csr.c:96]: BMU_EMPTY_INT (BMU @ p0x8c000). Pool ready. Jan 01 00:00:00.281 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2239]: Firmware .elf detected Jan 01 00:00:00.281 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2248]: Uploading CLASS firmware Jan 01 00:00:00.281 io_pkt_v6_hc.8 slog 0 INF[src/pfe_pe.c:609]: Selected FW loading OPs to load 8 PEs in parallel Jan 01 00:00:00.285 io_pkt_v6_hc.8 slog 0 INF[src/pfe_pe.c:1945]: pfe_ct.h file version"92367c0e25f21f49217a9b08168ad2c8" Jan 01 00:00:00.288 io_pkt_v6_hc.8 slog 0 INF[src/pfe_pe.c:2422]: [FW VERSION] 1.6.0, Build: Mar 15 2023, 12:37:54 (), ID: 0x31454650 Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 WRN[hw/s32g/pfe_platform_master.c:2312]: VLAN ID incorrect or not set. Using default VLAN ID = 0x01. Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 WRN[hw/s32g/pfe_platform_master.c:2318]: VLAN stats size incorrect or not set. Using default VLAN stats size = 20. Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 INF[src/pfe_l2br.c:1181]: Software vlan hash table @ p0x20001208 Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 INF[src/pfe_l2br.c:1286]: Fall-back bridge domain @ 0x20000a44 (class) Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 INF[src/pfe_l2br.c:1287]: Default bridge domain @ 0x20000a3c (class) Jan 01 00:00:00.406 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:2412]: Routing table created, Hash Table @ p0x80014000, Pool @ p0x8001c000 (65536 bytes) Jan 01 00:00:00.407 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_chnl.c:1997]: Initializing RX buffer pool. Depth: 256; Buffer Size: 2048; Cache Line Size: 64 Jan 01 00:00:00.408 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_chnl.c:1997]: Initializing RX buffer pool. Depth: 256; Buffer Size: 2048; Cache Line Size: 64 Jan 01 00:00:00.409 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_chnl.c:1997]: Initializing RX buffer pool. Depth: 256; Buffer Size: 2048; Cache Line Size: 64 Jan 01 00:00:00.508 io_pkt_v6_hc.8 slog 0 INF[hw/s32g/pfe_platform_master.c:3705]: Feature err051211_workaround: DISABLED Jan 01 00:00:00.509 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2145]: pfe0: Using static PHY mode, RESET=0 Jan 01 00:00:00.509 io_pkt_v6_hc.8 slog 0 INF[src/oal_irq_qnx.c:117]: PFE HIF0 IRQ Worker started (IRQ ID: 222) Jan 01 00:00:00.510 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1795]: Adding 00:0a:0b:0c:0d:66 to pfe0 Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2298]: Speed/duplex configuration for pfe0 not found. Using 1 Gbps/full-duplex. Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:336]: Attempt to register HIF client: 0 Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:1189]: HIF driver started Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2363]: New PFE device: 0, ID: 0 Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2145]: pfe1: Using static PHY mode, RESET=0 Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/oal_irq_qnx.c:117]: PFE HIF1 IRQ Worker started (IRQ ID: 223) Jan 01 00:00:00.512 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1795]: Adding 00:1a:1b:1c:1d:66 to pfe1 Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2298]: Speed/duplex configuration for pfe1 not found. Using 1 Gbps/full-duplex. Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:336]: Attempt to register HIF client: 1 Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:1189]: HIF driver started Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2363]: New PFE device: 1, ID: 2 Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2145]: pfe2: Using static PHY mode, RESET=0 Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/oal_irq_qnx.c:117]: PFE HIF2 IRQ Worker started (IRQ ID: 224) Jan 01 00:00:00.514 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:1795]: Adding 00:2a:2b:2c:2d:66 to pfe2 Jan 01 00:00:00.516 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2298]: Speed/duplex configuration for pfe2 not found. Using 1 Gbps/full-duplex. Jan 01 00:00:00.516 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:336]: Attempt to register HIF client: 2 Jan 01 00:00:00.516 io_pkt_v6_hc.8 slog 0 INF[src/pfe_hif_drv_sc.c:1189]: HIF driver started Jan 01 00:00:00.516 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2363]: New PFE device: 2, ID: 4 Jan 01 00:00:00.531 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2702]: Adding 00:0a:0b:0c:0d:66 to pfe0 Jan 01 00:00:00.531 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2707]: Unable to assign MAC address 00:0a:0b:0c:0d:66 to the pfe0 Jan 01 00:00:00.531 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode Jan 01 00:00:00.531 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2829]: EMAC speed change for SGMII is currently not supported. Jan 01 00:00:00.532 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0 Jan 01 00:00:00.534 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode Jan 01 00:00:00.534 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0 Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0 Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17 Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0 Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:00:00:00:01 into emac0: 17 Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0 Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17 Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2829]: EMAC speed change for SGMII is currently not supported. Jan 01 00:00:00.536 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 01:00:5e:00:00:01 to emac0 Jan 01 00:00:00.538 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0 Jan 01 00:00:00.538 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:00:00:00:01 into emac0: 17 Jan 01 00:00:00.538 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0 Jan 01 00:00:00.538 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17 Jan 01 00:00:00.538 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode Process 172057 (slog2info) exited status=0. Jan 01 00:01:01.630 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:00:00:00:01 to emac0 Jan 01 00:01:01.630 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:00:00:00:01 into emac0: 17 Jan 01 00:01:01.630 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2443]: Adding 33:33:ff:0c:0d:66 to emac0 Jan 01 00:01:01.630 io_pkt_v6_hc.8 slog 0 WRN[src/pfe_drv.c:2450]: unable to add 33:33:ff:0c:0d:66 into emac0: 17 Jan 01 00:01:01.630 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2495]: Removing 01:00:5e:00:00:01 from emac0 Jan 01 00:01:01.632 io_pkt_v6_hc.8 slog 0 INF[src/pfe_phy_if.c:2716]: Address 01:00:5e:00:00:01 removed from emac0 Jan 01 00:01:01.632 io_pkt_v6_hc.8 slog 0 INF[src/pfe_drv.c:2663]: pfe0: Disabling promiscuous mode Re: S32G399A-RDB3 QNX PFE Driver Problems Hello, @Seneca
Thanks for your post.
By default, the S32G PFE QNX Driver Version 1.4.0 is compatible with S32G PFE Firmware Standard Version 1.6.0, would you mind testing it again with this PFE FW version instead?
BR
Chenyin Re: S32G399A-RDB3 QNX PFE Driver Problems Ok, so I downloaded the BSP_nxp-s32g-evb_br-710_be-710_SVN984052_JBN51 package you mentioned, modified the .build file and add the kprintf("Reserving RAM region for PFE driver on EVB/RDB\n"); as_add_containing(0x80000000,0x80000000 + 0x4000000 - 1,AS_ATTR_RAM, "pfe_ddr","ram"); to src/hardware/startup/boards/s32g/s32g399a-rdb/s32g_init_raminfo.c and replace my ifs file with the resulting ifs-s32g399a-rdb.ui. Unfortunately, it doesn't seem to execute the pfe_ddr allocation from above. Is there anything I need to modify for the uboot parameters or else for this new image to work? Regards Re: S32G399A-RDB3 QNX PFE Driver Problems Hello, @Seneca
Thanks for your reply.
I suggest referencing the integration manual strictly, refer to the part you mentioned, the following need to be modified before building the QNX BSP.
chenyin_h_0-1782443542271.png
BR
Chenyin Re: S32G399A-RDB3 QNX PFE Driver Problems Greetings, do you know if NXP provides SDCard images that already have the uboot modifications necessary for PFE as in board_cleanup_before_linux? I don't know what packages like binaries_auto_linux_bsp37.0_s32g3_pfe do. Regards Re: S32G399A-RDB3 QNX PFE Driver Problems And what was the PFE firmware version used? JBN51 needs NXP BSP39 which comes with PFE Firmware 1.8.0. But section 2.1.3 of the Pfe Driver 1.7.0 release notes states that only PFW FW 1.10.0 was tested with this release. Seneca_0-1782903766239.png Re: S32G399A-RDB3 QNX PFE Driver Problems Hello, @Seneca
Thanks for your reply.
The tested BSP version is BSP39 combine with QNX driver version 1.7.0 and QNX SDP 7.1 BSP JBN51
BR
Chenyin Re: S32G399A-RDB3 QNX PFE Driver Problems Greetings, I intend to try the following combination: BSP 33 PFE Driver 1.2.0 PFE FW 1.3.0 Is this officially supported? Regards Re: S32G399A-RDB3 QNX PFE Driver Problems Greetings, I intend to try the following combination: BSP 33 PFE Driver 1.2.0 PFE FW 1.3.0 Is this officially supported? Regards Re: S32G399A-RDB3 QNX PFE Driver Problems Hello. @Seneca
Thanks for your reply.
1. For the combination, I suggest referencing the documents included in the QNX PFE drivers directly, which included the recommended/tested combination.
Other combination may or may not work, you may test it accordingly if indeed needed.
2. From the available information, for QNX PFE drive 1.2, the supported PFE FW is 1.2 with BSP30 used for test
BR
Chenyin Re: S32G399A-RDB3 QNX PFE Driver Problems Hello Chenyin, can you tell me which NXP BSP Version was used by the person who tested the PFE Driver 1.7.0 with the QNXJBN51? Regards Re: S32G399A-RDB3 QNX PFE Driver Problems Hello, @Seneca
Sorry that there are not such images for publicly downloaded.
For "binaries_auto_linux_bsp37.0_s32g3_pfe", seems it is the name of the tgz file from:
chenyin_h_0-1782879234963.png
If so, it includes the pre-built binaries of Linux BSP provisioned by NXP, there are not any QNX related images included.
BR
Chenyin Re: S32G399A-RDB3 QNX PFE Driver Problems Hello, @Seneca
Thanks for your reply.
Would you mind providing the full booting log including all u-boot env information for further checking?
BR
Chenyin Re: S32G399A-RDB3 QNX PFE Driver Problems Note: io pkt is not started at the moment. Starting it will not remove the no carrier problem though. U-Boot 2022.04 (Jul 01 2026 - 16:53:39 +0200) SoC: NXP S32G399A rev. 1.1 CPU: ARM Cortex-A53 r0p4 @ max 1300 MHz Model: NXP S32G399A-RDB3 DRAM: 3.5 GiB Core: 306 devices, 25 uclasses, devicetree: board MMC: FSL_SDHC: 0 Loading Environment from MMC... OK In: serial@401c8000 Out: serial@401c8000 Err: serial@401c8000 Board revision: RDB3 Revision F PCIe: BusDevFun VendorId DeviceId Device Class Sub-Class __________________________________________________________________________ pcie@40400000 RootComplex | `-- 01:00.00 0x1957 0x4300 Bridge device 0x04 Net: eth0: ethernet@4033c000 Found PFE version 0x0101 (S32G3) , eth1: pfe0, eth2: pfe1, eth3: pfe2 Hit any key to stop autoboot: 2 1 0 => printenv atf_fdt_0to3=fdt addr 0x83e00000; fdt resize; fdt set /cpus/cpu@1 cpu-release-addr <0x0 0xa0000010>; fdt set /cpus/cpu@100 cpu-release-addr <0x0 0xa0000010>; fdt set /cpus/cpu@101 cpu-release-addr <0x0 0xa0000010>; atf_fdt_4to7=fdt set /cpus/cpu@2 cpu-release-addr <0x0 0xa0000010>; fdt set /cpus/cpu@3 cpu-release-addr <0x0 0xa0000010>; fdt set /cpus/cpu@102 cpu-release-addr <0x0 0xa0000010>; fdt set /cpus/cpu@103 cpu-release-addr <0x0 0xa0000010>; baudrate=115200 board_rev=F boot_mtd=booti boot_qnx_atf=mmc dev 0; fatload mmc 0:1 0x83e00000 s32g399a-rdb3.dtb; run atf_fdt_0to3; run atf_fdt_4to7; fatload mmc 0:1 0x80080000 ifs-s32g399a-rdb.ui; bootm 0x80080000 - 0x83E00000 bootargs=root=/dev/ram rw earlycon loglevel=7 bootcmd=run boot_qnx_atf bootdelay=2 console=ttyLF0 cpu_trap=dcache off; mw.l 0xa0000000 0xd503205f; mw.l 0xa0000004 0x58000060; mw.l 0xa0000008 0xb4ffffc0; mw.l 0xa000000C 0xd61f0000; mw.q 0xa0000010 0x00000000; dcache on; eth1addr=00:04:9f:be:ef:00 eth2addr=00:04:9f:be:ef:01 eth3addr=00:04:9f:be:ef:02 ethaddr=0e:46:58:92:0b:68 fdt_addr=0x83000000 fdt_enable_hs400es=fdt addr ${fdt_addr}; fdt rm /soc/mmc no-1-8-v; fdt resize; fdt_file=s32g399a-rdb3.dtb fdt_high=0xffffffffffffffff fdt_override=; fdtcontroladdr=ffa96000 flashboot=echo Booting from flash...; run flashbootargs;mtd read Kernel ${loadaddr};mtd read DTB ${fdt_addr};mtd read Rootfs ${ramdisk_addr};${boot_mtd} ${loadaddr} ${ramdisk_addr} ${fdt_addr}; flashbootargs=setenv bootargs console=${console},${baudrate} root=/dev/ram rw earlycon ;setenv flashsize 0x04000000; hwconfig=serdes0:mode=pcie,clock=ext;pcie0:mode=rc;serdes1:mode=xpcs0&xpcs1,clock=ext,fmhz=125;xpcs1_0:speed=2G5;xpcs1_1:speed=1G image=Image initrd_high=0xffffffffffffffff ipaddr=10.0.0.100 loadaddr=0x80000000 loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}; run fdt_override; loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${image} loadtftpfdt=tftp ${fdt_addr} ${fdt_file}; loadtftpimage=tftp ${loadaddr} ${image}; mmcargs=setenv bootargs console=${console},${baudrate} root=${mmcroot} earlycon mmcboot=echo Booting from mmc ...; run mmcargs; if run loadfdt; then run fdt_fixups; ${boot_mtd} ${loadaddr} - ${fdt_addr}; else echo WARN: Cannot load the DT; fi; mmcdev=0 mmcpart=1 mmcroot=/dev/mmcblk0p2 rootwait rw netargs=setenv bootargs console=${console},${baudrate} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp earlycon netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${image}; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_file}; then ${boot_mtd} ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then ${boot_mtd}; else echo WARN: Cannot load the DT; fi; fi; else ${boot_mtd}; fi; netmask=255.255.255.0 nfsboot=echo Booting from net using tftp and nfs...; run nfsbootargs;run loadtftpimage; run loadtftpfdt;${boot_mtd} ${loadaddr} - ${fdt_addr}; nfsbootargs=setenv bootargs console=${console},${baudrate} root=/dev/nfs rw ip=${ipaddr}:${serverip}::${netmask}::eth0:off nfsroot=${serverip}:/tftpboot/rfs,nolock,v3,tcp earlycon pfe1_phy_addr=8 pfeng_mode=enable,sgmii,sgmii,rgmii ramdisk_addr=0x90000000 release_cpus=run cpu_trap; mp 1 release 0xa0000000; mp 2 release 0xa0000000; mp 3 release 0xa0000000; mp 4 release 0xa0000000; mp 5 release 0xa0000000; mp 6 release 0xa0000000; mp 7 release 0xa0000000; script=boot.scr serverip=10.0.0.1 skip_scmi_reset_agent=1 stderr=serial@401c8000 stdin=serial@401c8000 stdout=serial@401c8000 Environment size: 3581/8188 bytes => boot switch to partitions #0, OK mmc0 is current device 59970 bytes read in 7 ms (8.2 MiB/s) 9362112 bytes read in 394 ms (22.7 MiB/s) ## Booting kernel from Legacy Image at 80080000 ... Image Name: Image Type: AArch64 Linux Kernel Image (uncompressed) Data Size: 9362048 Bytes = 8.9 MiB Load Address: 80080000 Entry Point: 80080000 Verifying Checksum ... OK ## Flattened Device Tree blob at 83e00000 Booting using the fdt blob at 0x83e00000 Loading Kernel Image Using Device Tree in place at 0000000083e00000, end 0000000083e11fff fixup: pfe1: update phy addr to 0x8 Starting kernel ... board_cleanup_before_linux: QNX PFE code. ethernet@4033c000 Waiting for PHY auto negotiation to complete......... TIMEOUT ! phy_startup() failed: -110FAILED: -110 Found PFE version 0x0101 (S32G3) Found PFE version 0x0101 (S32G3) pfe2 Waiting for PHY auto negotiation to complete......... TIMEOUT ! pfeng_netif pfe1: Failed to establish XPCS link on PFE1 ## Setting pfe_ts clock ... ## Setting ftm0_sys clock ... ## Setting ftm0_ext clock ... ## Setting ftm1_sys clock ... ## Setting ftm1_ext clock ... Reserving RAM region for PFE driver on EVB/RDB ClockCycles samples: 0 166386615 1 166386614 2 166386615 3 166386615 4 166386615 5 166386615 6 166386616 7 166386615 All ClockCycles offsets within tolerance Welcome to QNX Neutrino 7.1.0 on the NXP S32G399A RDB Board!! Starting watchdog... Starting serial driver ... Starting Networking driver (/dev/socket)... Utarting SPI driver (/dev/spi0,1,2,3,4,5)... Starting I2C 0/1/2/3/4 driver (/dev/i2c0,1,2,3,4)... Starting USDHC0 memory card driver... [00] Starting QSPI Flash driver... SIM="SDMMC" HBA="imx" [00,0,0] type=00 ver=05 resp=00 SDMMC: Starting USB host driver (/dev/usb/*) Detected QSPI Flash: Macronix MX25UW512, JEDEC 0xC2 - 0x813A, Size: 0x4000000 Launching devb-umass for /dev/usb/* ... U# slogi 2info Jan 01 00:00:00.022 random.4 low* 0 qcrypto: loading configuration file '/etc/qcrypto.conf' [qcrypto_common.c(190)] Jan 01 00:00:00.023 random.4..0 slog* 700 Random is using the Fortuna PRNG Jan 01 00:00:00.031 random.4 low 0 qcrypto: 'openssl' plugin loaded [qcrypto_plugins.c(354)] Jan 01 00:00:00.031 random.4..0 slog 700 Selecting timer as an entropy source Jan 01 00:00:00.031 random.4..0 slog 700 Registered path names Jan 01 00:00:00.031 random.4..0 slog 700 random: starting resmgr Jan 01 00:00:00.031 random.4..0 slog 700 random: Daemonizing the process Jan 01 00:00:00.041 devc_serlinflexd.7 slog* 0 serlinflexd_interrupt_attach: Attaching to interrupt 114 Jan 01 00:00:10.146 spi_master.8 normal* 0 Starting spi-master resource manager Jan 01 00:00:10.149 spi_master.9 normal* 0 Starting spi-master resource manager Jan 01 00:00:10.152 spi_master.10 normal* 0 Starting spi-master resource manager Jan 01 00:00:10.155 spi_master.11 normal* 0 Starting spi-master resource manager Jan 01 00:00:10.158 spi_master.12 normal* 0 Starting spi-master resource manager Jan 01 00:00:10.161 spi_master.13 normal* 0 Starting spi-master resource manager Jan 01 00:00:10.177 devb_sdmmc_mx8x.19 slog* 1800 devb-sdmmc-mx8x 1.00A (Jul 1 2026 14:10:37) Jan 01 00:00:10.178 devb_sdmmc_mx8x.19 slog 0 libcam.so (Jun 22 2020 21:33:15) bver 7010003 Jan 01 00:00:10.189 devb_sdmmc_mx8x.19 slog 1800 sdio_cd: insertion path 0, cd state 0x1 Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 SD CID: Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 MID 0x27, OID 0x5048, PNM SD32G Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 PRV 0x62, PSN 0x6c62d196, MDT 4-2023 Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 SD CSD: Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 CSD_STRUCTURE 1, SPEC_VERS 0, CCC 0x5b5 Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 TAAC 14, NSAC 0, TRAN_SPEED 50 Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 C_SIZE 59023, C_SIZE_MULT 0 Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 READ_BL_LEN 9, WRITE_BL_LEN 9 Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 ERASE GRP_SIZE 0, GRP_MULT 0, SIZE 127 Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 blksz 512, sectors 60440576, dtr 25000000 Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 SD SW CAPS: Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 bus mode 0x3, cmd sys 0x1 Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 drv type 0x1, curr limit 0x1 Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 dtr 50000000 Jan 01 00:00:10.239 devb_sdmmc_mx8x.19 slog 1800 CFG: Timing HS, DTR 50000000, Bus Width 4 bit Jan 01 00:00:10.240 devb_sdmmc_mx8x.19 slog 100 cam-disk.so (Jun 22 2020 21:33:17) Jan 01 00:00:10.242 devb_sdmmc_mx8x.19 slog 0 scsi_interpret_sense (sdmmc ptl-0:0:0): cam_status=c4, scsi_status=2, flag=00000040, vuflag=0008, cmd=1a, error=70, sense=5, asc=24, ascq=0 Jan 01 00:00:10.242 devb_sdmmc_mx8x.19 slog 0 scsi_interpret_sense (sdmmc ptl-0:0:0): cam_status=c4, scsi_status=2, flag=00000040, vuflag=0008, cmd=5a, error=70, sense=5, asc=24, ascq=0 Jan 01 00:00:10.242 devb_sdmmc_mx8x.19 slog 0 scsi_interpret_sense (sdmmc ptl-0:0:0): cam_status=c4, scsi_status=2, flag=00000040, vuflag=0008, cmd=5a, error=70, sense=5, asc=24, ascq=0 Jan 01 00:00:10.248 io_usb_otg.21 slog* 0 main(453)[tid:1]: io-usb-otg (Jun 13 2020 20:10:17) args: -d hcd-ehci-mx28 ioport=0x44064100,irq=243,ulpi,no_stream,verbose=5 Jan 01 00:00:10.250 devf_qspi_s32g.20 slog* 0 (devf t1::f3s_qspi_ident:73) Page size: 256 Jan 01 00:00:10.250 devf_qspi_s32g.20 slog 0 (devf t1::f3s_qspi_ident:74) Total chip size: 0x4000000, Unit size: 0x10000 Jan 01 00:00:10.254 io_usb_otg.21 slog 0 ehci_init: Initialiaing with sever version: 2 Jan 01 00:00:10.254 io_usb_otg.21 slog 0 ehci_controller_init(4292): devu-hcd-ehci-mx28.so (Aug 15 2023 16:44:48): args ulpi,no_stream,verbose=5 Jan 01 00:00:10.254 io_usb_otg.21 slog 8 usb_enum_port(94)[tid:1]: busno 0, parent -1, port 0, High speed Jan 01 00:00:10.255 io_usb_otg.21 slog 11 usb_client_descriptor_get(198)[tid:1]: (type 1, index 0, length 😎 Jan 01 00:00:10.255 io_usb_otg.21 slog 12 usb_device_set_address(245)[tid:1]: b:0 devno 0 Jan 01 00:00:10.255 io_usb_otg.21 slog 11 usb_client_descriptor_get(198)[tid:1]: (type 1, index 0, length 18) Jan 01 00:00:10.255 io_usb_otg.21 slog 11 usb_client_descriptor_get(198)[tid:1]: (type 2, index 0, length 9) Jan 01 00:00:10.255 io_usb_otg.21 slog 11 usb_client_descriptor_get(198)[tid:1]: (type 2, index 0, length 25) Jan 01 00:00:10.256 io_usb_otg.21 slog 8 usb_enum_port(141)[tid:1]: vid 0x0000, did 0x0000 enumerated(busno 0, devno 0:0) Jan 01 00:00:10.256 io_usb_otg.21 slog 11 hub_state_inserted(569)[tid:1]: bdentry 0, dentry 0 0 Jan 01 00:00:10.256 io_usb_otg.21 slog 13 hub_configuration_enable(263)[tid:1]: 1 Jan 01 00:00:10.358 io_usb_otg.21 slog 0 usbh_timeout_init(203)[tid:1]: Complete Jan 01 00:00:10.369 io_usb_otg.21 slog 0 read_vid_pid: ULPI VID 0x0424 PID 0x0009 Jan 01 00:00:10.369 io_usb_otg.21 slog 0 s32g_phy_set_vbus: set_vbus off Jan 01 00:00:10.383 io_usb_otg.21 slog 0 s32g_phy_set_vbus: set_vbus on Jan 01 00:00:10.394 io_usb_otg.21 slog 0 ehci_get_port_status(3557 0x44064100): port=0, tpstatus 10100 e_pstatus 8c001000 Jan 01 00:00:10.394 io_usb_otg.21 slog 8 usb_enum_port_extract(172)[tid:7]: (busno 0, pdevno 0, portno 1) Jan 01 00:00:10.394 io_usb_otg.21 slog 8 usb_enum_port_extract(192)[tid:7]: status (2) Jan 01 00:00:10.398 devb_umass.22 slog* 900 devb-umass 1.00A (Jun 22 2020 21:33:41) Jan 01 00:00:10.399 devb_umass.22 slog 0 libcam.so (Jun 22 2020 21:33:15) bver 7010003 Jan 01 00:00:10.400 io_usb_otg.21 slog 0 usbdi_client_connect(58)[tid:5]: pid 22 proc=proc/boot/devb-umass usbdi_client 51ba29fa80 Jan 01 00:00:10.400 io_usb_otg.21 slog 0 usbdi_resmgr_connect(310)[tid:5]: usbdi_resmgr_connect: pid 22 usbdi_client 51ba29fa80 Jan 01 00:00:10.400 devb_umass.22 slog 0 usbdi debug path /pps/usb/debug/ doesn't exist Jan 01 00:00:14.507 qconn.24 slog* 0 Couldn't initialize listen service: tcp (Address family not supported by protocol family) Re: S32G399A-RDB3 QNX PFE Driver Problems Hello, @Seneca
Thanks for sharing the log.
There seems serdes issues existed during the booting phase, may I know if you had done the following modification? (to comment out the init_serdes() function)
chenyin_h_0-1782977121730.png
BR
Chenyin Re: S32G399A-RDB3 QNX PFE Driver Problems Note: I not both pfe0 and pfe2 work at the same time. And when I ping them from an external machine it assigns pfe0 a funny mac address: arp -a | grep 192 ? (192.168.0.200) at 22:33:44:55:66:77 [ether] on enx00e04c680383 ? (192.168.0.202) at on enx00e04c680383 This is from qnx slog2info: Jan 01 00:00:58.251 iopkt.4121 main_buffer 0 duplicate IP address 192.168.0.200 sent from link address 22:33:44:55:66:77 Re: S32G399A-RDB3 QNX PFE Driver Problems Ok some more news: When I start the network client manually io-pkt-v6-hc -p tcpip pkt_typed_mem=pfe_ddr -d /proc/boot/devnp-pfe-2.so pfe0_mac=000a0b0c0d66,pfe1_mac=001a1b1c1d66,pfe2_mac=002a2b2c2d66,class_fw=/proc/boot/s32g_pfe_class.fw,util_fw=/proc/boot/s32g_pfe_util.fw and set a static ip for pfe0 ifconfig pfe0 192.168.0.200 netmask 255.255.255.0 ifconfig pfe0 down ifconfig pfe0 up I actually get a ping to an external address. Nevertheless, in ifconfig pfe0 still shows ethernet none. It seems to me there are problems negotiating interface speed # slog2info | grep pfe0 Jan 01 00:00:25.515 iopkt.4121 main_buffer 0 /proc/boot/devnp-pfe-2.so pfe0_mac=000a0b0c0d66,pfe1_mac=001a1b1c1d66,pfe2_mac=002a2b2c2d66,class_fw=/proc/boot/s32g_pfe_class.fw,util_fw=/proc/boot/s32g_pfe_util.fw Jan 01 00:00:25.517 io_pkt_v6_hc.4121 slog 0 INF[src/pfe_drv.c:1460]: MII mode configuration for pfe0/EMAC0 not found. Using SGMII. Jan 01 00:00:25.647 iopkt.4121 main_buffer 0 pfe0 Process 98332 (slog2info) exited status=0. Jan 01 00:00:25.647 io_pkt_v6_hc.4121 slog 0 INF[src/pfe_drv.c:2124]: pfe0: Using static PHY mode, RESET=0 Jan 01 00:00:25.647 io_pkt_v6_hc.4121 slog 0 INF[src/pfe_drv.c:2286]: Speed/duplex configuration for pfe0 not found. Using 1 Gbps/full-duplex. Jan 01 00:00:58.251 io_pkt_v6_hc.4121 slog 0 INF[src/pfe_drv.c:2606]: pfe0: Disabling promiscuous mode Jan 01 00:00:58.251 io_pkt_v6_hc.4121 slog 0 INF[src/pfe_drv.c:2606]: pfe0: Disabling promiscuous mode Jan 01 00:00:58.251 io_pkt_v6_hc.4121 slog 0 INF[src/pfe_drv.c:2606]: pfe0: Disabling promiscuous mode Jan 01 00:00:58.251 io_pkt_v6_hc.4121 slog 0 INF[src/pfe_drv.c:2606]: pfe0: Disabling promiscuous mode Jan 01 00:01:05.966 io_pkt_v6_hc.4121 slog 0 INF[src/pfe_drv.c:2606]: pfe0: Disabling promiscuous mode For Pfe2 it might already fail in uboot in the board_cleanup_before_linux pfe2 Waiting for PHY auto negotiation to complete......... TIMEOUT ! Edit: I can also obtain a ping from pfe2 but it also seems to have problems negotiating the correct speed. I wonder if the above timeout is correct. Re: S32G399A-RDB3 QNX PFE Driver Problems Ok then hopefully these questions will bring me close to the finish line: - How should I set the MAC addresses of pfe0 and pfe2? I understand an attempt is made to set it via io pkt io-pkt-v6-hc -p tcpip pkt_typed_mem=pfe_ddr -d /proc/boot/devnp-pfe-2.so pfe0_mac=000a0b0c0d66,pfe1_mac=001a1b1c1d66,pfe2_mac=002a2b2c2d66,class_fw=/proc/boot/s32g_pfe_class.fw,util_fw=/proc/boot/s32g_pfe_util.fw But when I ping pfe0 from an external machine that machines arp table presents a bogus address ? (192.168.0.200) at 22:33:44:55:66:77 [ether] on enx00e04c680383 On the external machine, tcpdump reveals there doesn't seem to be an arp response from pfe0 which has 192.168.0.200: 08:53:11.208021 IP6 user-Precision-7510 > ff02::16: HBH ICMP6, multicast listener report v2, 2 group record(s), length 48 08:53:11.394038 IP6 user-Precision-7510 > ff02::16: HBH ICMP6, multicast listener report v2, 2 group record(s), length 48 08:53:25.750284 ARP, Request who-has 192.168.0.200 tell 192.168.0.200, length 46 08:53:26.641915 IP6 :: > ff02::1:ff0c:d66: HBH ICMP6, multicast listener reportmax resp delay: 0 addr: ff02::1:ff0c:d66, length 24 08:53:26.692011 IP6 :: > ff02::1:ff0c:d66: ICMP6, neighbor solicitation, who has fe80::20a:bff:fe0c:d66, length 24 08:53:32.742005 IP6 fe80::20a:bff:fe0c:d66 > ff02::1:ff0c:d66: HBH ICMP6, multicast listener reportmax resp delay: 0 addr: ff02::1:ff0c:d66, length 24 When I cast another ping from the external machine I finally get a response: 08:59:22.118282 ARP, Request who-has 192.168.0.200 tell user-Precision-7510, length 28 08:59:22.118553 ARP, Reply 192.168.0.200 is-at 22:33:44:55:66:77 (oui Unknown), length 46 08:59:22.118569 IP user-Precision-7510 > 192.168.0.200: ICMP echo request, id 1, seq 1, length 64 08:59:22.118554 ARP, Reply 192.168.0.200 is-at 00:0a:0b:0c:0d:66 (oui Unknown), length 46 00:0a:0b:0c:0d:66 is what should be the correct mac address. Nevertheless the arp table of the external machine still shows the bogus address arp -a ? (192.168.0.200) at 22:33:44:55:66:77 [ether] on enx00e04c680383 My first guess would be to set them manually in uboot but I see no section in the integration manual that recommends that. - What are the commands to use "fixed link"? Regards Re: S32G399A-RDB3 QNX PFE Driver Problems I see. The ethaddr, eth1addr, eth2addr, eth3addr are set in my uboot but they are not enough to prevent the funny MAC for pfe0. Are there other parameters? Re: S32G399A-RDB3 QNX PFE Driver Problems Hello, @Seneca
Thanks for your updates.
Glad that the PFE would ping correctly with the external machine.
There are limitation for the PFE driver in QNX:
chenyin_h_0-1783044213433.png
So that it is suggested using the fixed link, while speed changes triggered by AN are not supported.
BR
Chenyin Re: S32G399A-RDB3 QNX PFE Driver Problems Ok, just for understanding this right: There is another component that just happens to use 192.168.0.200? And if I use 192.168.1.200 for pfe0 I will be fine? Regards Re: S32G399A-RDB3 QNX PFE Driver Problems Hello, @Seneca
Thanks for the reply.
1. Yes, it is usually by default used by the switch connected.
2. I think the new IP addr you mentioned is fine for the test.
BR
Chenyin Re: S32G399A-RDB3 QNX PFE Driver Problems Hello, @Seneca
Thanks for your reply.
1. For setting the MAC address, you may try using the "io-pkt-v6-hc -p tcpip -d \ pfe1_mac=000a0b0c0d0e,pfe2_mac=001a1b1c1d1e" for example.
2. Since you are using RDB3, while with default settings you tried, the PFE0 connected to the sja1110 switch, usually the 192.168.0.200 is set internally within the SJA1110 SDK, so I suggest not using this IP for testing with PFE0, you may try setting other IP address like 192.168.1.X for PFE0
3. In u-boot, you may try setting the mac address with the "setenv ethaddr/eth1addr/eth2addr xxxx" for each MAC.
BR
Chenyin Re: S32G399A-RDB3 QNX PFE Driver Problems Greetings chenyin, I intend to create a bridge interface using the ethernet ports gmac0, pfe0, pfe2. https://www.qnx.com/developers/docs/7.0.0/index.html#com.qnx.doc.neutrino.utilities/topic/b/brconfig.html The connected clients are intended to be in the subnet 192.168.0.X netmask 255.255.255.0 Will this conflict with 192.168.0.200 or anything else? Regards Re: S32G399A-RDB3 QNX PFE Driver Problems Hello, @Seneca
Thanks for your reply.
If you do want to use the 192.168,.0.x subnet, when not assigning 192.168.0.200 to both PFE0 and the external devices that are connected to the switch, It would be correct for the network connection when you try pinging from outside to PFE0 or vice versa.
BR
Chenyin
Re: S32G399A-RDB3 QNX PFE Driver Problems Hello, @Seneca
Thanks for your reply.
From my understanding, there would not be confliction while not using 192.168.0.200.
However, if possible, you may use other subnet instead to avoid possible issues.
BR
Chenyin Re: S32G399A-RDB3 QNX PFE Driver Problems Greetings, can you tell me if 192.168.0.200 listens to broadcast calls or something like that? Regards Re: S32G399A-RDB3 QNX PFE Driver Problems Would you mind making sure internally? Is there anything 192.168.0.200 does that requires it to have sole control of the subnet? Re: S32G399A-RDB3 QNX PFE Driver Problems Hello, @Seneca
Thanks for your reply.
This IP could receive the broadcast packets from linked devices.
BR
Chenyin Re: S32G399A-RDB3 QNX PFE Driver Problems Greetings chenyin, a new problem has arisen: The arp handshake fails when I connect a TC387 / FreeRTOS target to pfe_mac2. It works with a regular Linux machine. Any ideas? Re: S32G399A-RDB3 QNX PFE Driver Problems Hello, @Seneca
Thanks for your reply.
Since the same setup works with a Linux machine, the problem is more likely to be on the TC387 side (Ethernet driver, TCP/IP stack configuration, or related implementation) rather than on the MAC side. Further packet-level analysis would be needed to confirm the exact cause
BR
Chenyin Re: S32G399A-RDB3 QNX PFE Driver Problems Hello, @Seneca
Thanks for your reply.
Since the PFE2 could work correctly with a Linux machine, there may not much issue existed on the S32G side, in order for solving your issue, you may try checking the link status, every frames sent between the two sides and then analyze on them, sorry that I do not know much about the software stack on your Infineon board.
BR
Chenyin Re: S32G399A-RDB3 QNX PFE Driver Problems Greetings, when I connect the TC387 to my Linux desktop there are lots of arp/icmp messages produced immediately. The same when I connect my S32G pfe2 port to the Linux desktop. But when I connect the TC387 to the S32G pfe2 port I get not arp or icmp messages at all. For which error messages should I look? Regards Re: S32G399A-RDB3 QNX PFE Driver Problems Greetings chenyin, could you please tell me again which ports on the target was exactly pfe0 and pfe2 on s32g399Ardb3? I assumed pfe0 is the left one of the three stacked ports and pfe2 top-center, is this correct? Are there any known problems mixing pfe and gmac? Regards Re: S32G399A-RDB3 QNX PFE Driver Problems Hello, @Seneca
Thanks for your reply. I suggest referencing the following picture.
chenyin_h_0-1784081687384.png
PFE0 is connected with the SJA1110, cables connected to P1/2/3 could be linked with PFE0
GMAC could be used with PFE together.
BR
Chenyin Re: S32G399A-RDB3 QNX PFE Driver Problems Another thing. Will this uboot line recommended in the integration manual: hwconfig "serdes0:mode=pcie,clock=ext;pcie0:mode=rc;serdes1:mode=xpcs0&xpcs1,clock=ext,fmhz=125;xpcs1_0:speed=2G5;xpcs1_1:speed=1G" Really enable gmac0, pfe0 and pfe2 as individual interfaces or only two of them? Re: S32G399A-RDB3 QNX PFE Driver Problems Hello, @Seneca
Thanks for your reply.
1. For the hwconfig you mentioned, when using them on RDB3, the 3 MACs could all be used.
2. For the error log you shared, sorry that we do not commonly support QNX commands directly, form my personal experience, it may caused by the command used itself, I suggest re-checking syntax of commands based on the QNX document.
3. Under QNX, there are some limitation for the PFE driver, auto-negotiation is not supported, so you may make sure that the two sides are running with the same speed.
chenyin_h_0-1784104171784.png
BR
Chenyin Re: S32G399A-RDB3 QNX PFE Driver Problems Greetings, I tried setting the correct speed on QNX with something like ifconfig pfe2 media 100baseTX mediaopt full-duplex but it wasn't enough. Do I have to do something else, maybe even in uboot parameters? Regards Re: S32G399A-RDB3 QNX PFE Driver Problems Greetings, after more research it seem that pfe_mac2 in particular has problems with our 100T1 ethernet adapters. Connecting a Linux Laptop with USB ethernet works fine though. Do you know if pfe_mac2 can connect to this adapter type correctly and if I have to do something special to make it work? Regards Re: S32G399A-RDB3 QNX PFE Driver Problems Ok, so I should be able to use, from the three stacked ports, left port as pfe0 and top center as pfe2 I presume. Bottom center for gmac0. Now, I try to start the interfaces in bridge mode using the following io pkt syntax (note the bridge parameter behind tcp ip): io-pkt-v6-hc -p tcpip bridge pkt_typed_mem=pfe_ddr -d dwceqos-s32g mac=`genmac-random -m`,ptp_off,verbose=5 -d /proc/boot/devnp-pfe-2.so pfe0_mac=000a0b0c0d66,pfe1_mac=001a1b1c1d66,pfe2_mac=002a2b2c2d66,class_fw=/proc/boot/s32g_pfe_class.fw,util_fw=/proc/boot/s32g_pfe_util.fw ifconfig dwc0 192.168.10.100 up ifconfig pfe0 0.0.0.0 up ifconfig pfe2 0.0.0.0 up ifconfig bridge0 create ifconfig bridge0 add dwc0 add pfe0 add pfe2 up This will result in lots of memory errors in slog2info Jan 01 00:04:37.485 io_pkt_v6_hc.159753 slog 0 ERR[src/pfe_drv.c:2996]: (DRIVER) event 1 - Driver runtime error: Mbuf addr out of 32bit. Start @ p0x8df239b58 end @ p0x8df239b82 Jan 01 00:04:38.485 io_pkt_v6_hc.159753 slog 0 ERR[src/pfe_drv.c:2996]: (DRIVER) event 1 - Driver runtime error: Mbuf addr out of 32bit. Start @ p0x8df239558 end @ p0x8df239582 Jan 01 00:04:38.485 io_pkt_v6_hc.159753 slog 0 ERR[src/pfe_drv.c:2996]: (DRIVER) event 1 - Driver runtime error: Mbuf addr out of 32bit. Start @ p0x8df239558 end @ p0x8df239582 Jan 01 00:04:39.451 io_pkt_v6_hc.159753 slog 0 ERR[src/pfe_drv.c:2996]: (DRIVER) event 1 - Driver runtime error: Mbuf addr out of 32bit. Start @ p0x8df239b58 end @ p0x8df239b82 Jan 01 00:04:39.451 io_pkt_v6_hc.159753 slog 0 ERR[src/pfe_drv.c:2996]: (DRIVER) event 1 - Driver runtime error: Mbuf addr out of 32bit. Start @ p0x8df239b58 end @ p0x8df239b82 Is bridge parameter correct in io-pkt-v6-hc call? Also, I use this allocation from the driver integration manual for both gmac0 and pfe as can be seen in the io-pkt-v6-hc call. Is that a problem? kprintf("Reserving RAM region for PFE driver on EVB/RDB\n"); as_add_containing(0x80000000,0x80000000 + 0x4000000 - 1,AS_ATTR_RAM, "pfe_ddr","ram"); Re: S32G399A-RDB3 QNX PFE Driver Problems Hello, @Seneca
Thanks for your post.
1. I can confirm that the PFE2 port on RDB3 could work correctly with connection to 100T1 network via a 100base-TX<->100base-T1 converter under Linux BSP provisioned by NXP.
2. You may try the following command for a test: io-pkt-v6-hc -p tcpip -d pfe2_link=100-1-2
But I am not very sure for these settings on QNX since it is beyond our S32G community supporting scope, sorry for your inconvenience.
BR
Chenyin
查看全文