Issue "Weston.Service" on the "imx95-15x15-frdm" Debian using flex-installer "lsdk2606" version Hello, I installed the Debian image using flex-installer version "lsdk2606" using Spoiler (Highlight to read) sudo flex-installer -i auto -d /dev/sdX -m imx95-15x15-frdm sudo flex-installer -i auto -d /dev/sdX -m imx95-15x15-frdm on my imx95-15x15-frdm Then, I followed the standard procedure to continue the installation using Spoiler (Highlight to read) debian-post-install-pkg debian-post-install-pkg After installing all the packages and rebooting, I encounter this error at startup: Spoiler (Highlight to read) [FAILED] Failed to start weston.service - W…nd compositor, as a system service. [FAILED] Failed to start weston.service - W…nd compositor, as a system service. Spoiler (Highlight to read) root@imx95-15x15-frdm:~# systemctl status weston.service × weston.service - Weston, a Wayland compositor, as a system service Loaded: loaded (/usr/lib/systemd/system/weston.service; enabled; preset: enabled) Active: failed (Result: exit-code) since Mon 2026-07-20 13:51:20 UTC; 19s ago Invocation: 67b22b0fa1484ce681d8b2acdc107add TriggeredBy: ● weston.socket Docs: man:weston(1) man:weston.ini(5) http://wayland.freedesktop.org/ Process: 408 ExecStart=/usr/bin/weston --log=${XDG_RUNTIME_DIR}/weston.log --modules=systemd-notify.so (code=exited, status=1/FAILURE) Main PID: 408 (code=exited, status=1/FAILURE) Mem peak: 3.5M CPU: 49ms Jul 20 13:51:19 imx95-15x15-frdm systemd[1]: Starting weston.service - Weston, a Wayland compositor, as a system service... Jul 20 13:51:19 imx95-15x15-frdm (weston)[408]: pam_unix(weston-autologin:session): session opened for user root(uid=0) by (uid=0) Jul 20 13:51:20 imx95-15x15-frdm systemd[1]: weston.service: Main process exited, code=exited, status=1/FAILURE Jul 20 13:51:20 imx95-15x15-frdm systemd[1]: weston.service: Failed with result 'exit-code'. Jul 20 13:51:20 imx95-15x15-frdm systemd[1]: Failed to start weston.service - Weston, a Wayland compositor, as a system service. root@imx95-15x15-frdm:~# systemctl status weston.service× weston.service - Weston, a Wayland compositor, as a system service Loaded: loaded (/usr/lib/systemd/system/weston.service; enabled; preset: enabled) Active: failed (Result: exit-code) since Mon 2026-07-20 13:51:20 UTC; 19s ago Invocation: 67b22b0fa1484ce681d8b2acdc107addTriggeredBy: ● weston.socket Docs: man:weston(1) man:weston.ini(5) http://wayland.freedesktop.org/ Process: 408 ExecStart=/usr/bin/weston --log=${XDG_RUNTIME_DIR}/weston.log --modules=systemd-notify.so (code=exited, status=1/FAILURE) Main PID: 408 (code=exited, status=1/FAILURE) Mem peak: 3.5M CPU: 49ms Jul 20 13:51:19 imx95-15x15-frdm systemd[1]: Starting weston.service - Weston, a Wayland compositor, as a system service...Jul 20 13:51:19 imx95-15x15-frdm (weston)[408]: pam_unix(weston-autologin:session): session opened for user root(uid=0) by (uid=0)Jul 20 13:51:20 imx95-15x15-frdm systemd[1]: weston.service: Main process exited, code=exited, status=1/FAILUREJul 20 13:51:20 imx95-15x15-frdm systemd[1]: weston.service: Failed with result 'exit-code'.Jul 20 13:51:20 imx95-15x15-frdm systemd[1]: Failed to start weston.service - Weston, a Wayland compositor, as a system service. Spoiler (Highlight to read) root@imx95-15x15-frdm:~# cat /run/user/0/weston.log Date: 2026-07-20 UTC [12:34:22.150] weston 14.0.2 https://wayland.freedesktop.org Bug reports to: https://gitlab.freedesktop.org/wayland/weston/issues/ Build: LSDK-25.12_DEBIAN-13_LF-6.12.20-168-g2ddc741+ [12:34:22.153] Command line: /usr/bin/weston --log=/run/user/0/weston.log --modules=systemd-notify.so [12:34:22.153] OS: Linux, 6.12.49, #5 SMP PREEMPT Thu May 28 13:07:26 KST 2026, aarch64 [12:34:22.153] Flight recorder: enabled [12:34:22.155] Using config file '/etc/xdg/weston/weston.ini' [12:34:22.156] Output repaint window is 16 ms maximum. [12:34:22.158] Loading module '/usr/lib/libweston-14/drm-backend.so' [12:34:22.162] Failed to load module: libdisplay-info.so.1: cannot open shared object file: No such file or directory [12:34:22.162] fatal: failed to create compositor backend root@imx95-15x15-frdm:~# cat /run/user/0/weston.logDate: 2026-07-20 UTC[12:34:22.150] weston 14.0.2https://wayland.freedesktop.orgBug reports to: https://gitlab.freedesktop.org/wayland/weston/issues/Build: LSDK-25.12_DEBIAN-13_LF-6.12.20-168-g2ddc741+[12:34:22.153] Command line: /usr/bin/weston --log=/run/user/0/weston.log --modules=systemd-notify.so[12:34:22.153] OS: Linux, 6.12.49, #5 SMP PREEMPT Thu May 28 13:07:26 KST 2026, aarch64[12:34:22.153] Flight recorder: enabled[12:34:22.155] Using config file '/etc/xdg/weston/weston.ini'[12:34:22.156] Output repaint window is 16 ms maximum.[12:34:22.158] Loading module '/usr/lib/libweston-14/drm-backend.so'[12:34:22.162] Failed to load module: libdisplay-info.so.1: cannot open shared object file: No such file or directory[12:34:22.162] fatal: failed to create compositor backend I'm getting this error too (I don't know if it's related), but nothing is showing up on my screen. Spoiler (Highlight to read) it6263 3-004c: failed to clear DDC FIFO it6263 3-004c: Failed to read EDID it6263 3-004c: failed to clear DDC FIFOit6263 3-004c: Failed to read EDID Re: Issue "Weston.Service" on the "imx95-15x15-frdm" Debian using flex-installe root@imx95-15x15-frdm:~# ldd /usr/lib/libweston-14/drm-backend.so linux-vdso.so.1 (0x0000ffffac56c000) libweston-14.so.0 => /usr/lib/libweston-14.so.0 (0x0000ffffac410000) libwayland-client.so.0 => /lib/aarch64-linux-gnu/libwayland-client.so.0 (0x0000ffffac3e0000) libpixman-1.so.0 => /lib/aarch64-linux-gnu/libpixman-1.so.0 (0x0000ffffac330000) libwayland-server.so.0 => /lib/aarch64-linux-gnu/libwayland-server.so.0 (0x0000ffffac2f0000) libdrm.so.2 => /usr/lib/libdrm.so.2 (0x0000ffffac2b0000) libudev.so.1 => /lib/aarch64-linux-gnu/libudev.so.1 (0x0000ffffac250000) libdisplay-info.so.1 => not found libgbm.so.1 => /usr/lib/libgbm.so.1 (0x0000ffffac220000) libseat.so.1 => /lib/aarch64-linux-gnu/libseat.so.1 (0x0000ffffac1f0000) libinput.so.10 => /lib/aarch64-linux-gnu/libinput.so.10 (0x0000ffffac170000) libc.so.6 => /lib/aarch64-linux-gnu/libc.so.6 (0x0000ffffabfb0000) /lib/ld-linux-aarch64.so.1 (0x0000ffffac520000) libxkbcommon.so.0 => /lib/aarch64-linux-gnu/libxkbcommon.so.0 (0x0000ffffabf40000) libffi.so.8 => /lib/aarch64-linux-gnu/libffi.so.8 (0x0000ffffabf10000) libm.so.6 => /lib/aarch64-linux-gnu/libm.so.6 (0x0000ffffabe60000) libcap.so.2 => /lib/aarch64-linux-gnu/libcap.so.2 (0x0000ffffabe30000) libsystemd.so.0 => /lib/aarch64-linux-gnu/libsystemd.so.0 (0x0000ffffabd00000) libmtdev.so.1 => /lib/aarch64-linux-gnu/libmtdev.so.1 (0x0000ffffabcd0000) libevdev.so.2 => /lib/aarch64-linux-gnu/libevdev.so.2 (0x0000ffffabc90000) libwacom.so.9 => /lib/aarch64-linux-gnu/libwacom.so.9 (0x0000ffffabc60000) libgudev-1.0.so.0 => /lib/aarch64-linux-gnu/libgudev-1.0.so.0 (0x0000ffffabc30000) libgobject-2.0.so.0 => /lib/aarch64-linux-gnu/libgobject-2.0.so.0 (0x0000ffffabba0000) libglib-2.0.so.0 => /lib/aarch64-linux-gnu/libglib-2.0.so.0 (0x0000ffffaba10000) libatomic.so.1 => /lib/aarch64-linux-gnu/libatomic.so.1 (0x0000ffffab9e0000) libpcre2-8.so.0 => /lib/aarch64-linux-gnu/libpcre2-8.so.0 (0x0000ffffab920000) Re: Issue "Weston.Service" on the "imx95-15x15-frdm" Debian using flex-installe Thank you for the update.
I can see that libdisplay-info is present on the system, but the Weston log is looking for libdisplay-info.so.1, while the installed library appears to be libdisplay-info.so.2.
Could you please run the following command and share the output?
ldd /usr/lib/libweston-14/drm-backend.so
This will help verify whether there is a library version mismatch or another missing dependency. Re: Issue "Weston.Service" on the "imx95-15x15-frdm" Debian using flex-installe Could you please run the following command and share the output?
find /usr -name "libdisplay-info*"
Thanks Re: Issue "Weston.Service" on the "imx95-15x15-frdm" Debian using flex-installe Hello root@imx95-15x15-frdm:~# find /usr -name "libdisplay-info*" /usr/lib/aarch64-linux-gnu/libdisplay-info.so.2 /usr/lib/aarch64-linux-gnu/libdisplay-info.so.0.2.0 /usr/share/doc/libdisplay-info2
View full article