2351388_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2351388_en-US

2351388_en-US

S32K344/358/388 SWO Printf not work is S32DS3.6

Hi Team,

I have tested the SWO printf function with pe multilink and S32DS3.6 following this step.  I have used the S32K3 official EVB and checked the SWO pin have extended out successfully. The S32K311,312 SWO can work fine, but S32K344,358,388 can't print out. There must be some hidden settings which needs to be done in the software, Could you help to test and try?

I have tested S32DS3.6.1, 3.6.2, 3.6.3, 3.6.5. All behaves the same, 311/312 can work fine and 344,358,388 can't work.

Jeremy_He_0-1776246390000.png


Priority: HIGHS32DSRe: S32K344/358/388 SWO Printf not work is S32DS3.6

I have checked the RM for the SWO routing for S32K344 and 312. 344 is more complex.  Maybe some extra switch need to be swited on by software.

Jeremy_He_0-1776247696494.png



Jeremy_He_1-1776247702054.png




Best Regards,

Jeremy

Re: S32K344/358/388 SWO Printf not work is S32DS3.6

Hi Jeremy, 

I'll look at your issue. In past it was known bug, but hope that it is fixed now. Are you using latest PE Micro plugin? 

Re: S32K344/358/388 SWO Printf not work is S32DS3.6

Hi jiri,


This is my PE micro plugin

Jeremy_He_0-1778722651976.png


Re: S32K344/358/388 SWO Printf not work is S32DS3.6

Hi Jiri,

I will test it when I get time lator? Have you tried this  v6.1.8 version? 


Best Regards,

Jeremy

Re: S32K344/358/388 SWO Printf not work is S32DS3.6

Hi Jeremy, 

please try to use the latest PE Micro plugin which is v6.1.8

Re: S32K344/358/388 SWO Printf not work is S32DS3.6

Hi Jiri, this issue still exists at my side, any update on your side?


Best Regards,

Jermey

Tags (1)
No ratings
Version history
Last update:
‎07-24-2026 04:31 AM
Updated by: