Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
如何在不再次受骗的情况下找回丢失的比特币 我从未想过自己会成为加密货币投资骗局的受害者。和许多其他人一样,我被承诺高回报,并相信我的投资是安全的。原本很有前途的加密货币投资,很快就变成了我经历过的最痛苦的事情之一。和许多寻求财务增长和保障的人一样,我信任了一个看似合法的投资平台。网站看起来很专业,客服代表也很有说服力,而且很真诚。随着时间的推移,我总共投资了 21 万欧元购买比特币,相信这样能为自己和家人创造更美好的未来。然后,毫无预兆地,一切都变了。当我尝试提现资金时,遇到了各种延误、借口和要求额外付款的情况。此后不久,通讯彻底中断。我痛苦地意识到,我成了精心设计的骗局的受害者。情感上的冲击是巨大的。我感到被背叛、羞辱和崩溃。我辛辛苦苦挣来的钱没了,随之而来的还有我的自信和内心的平静,无数次的自责,以及越来越强烈的恐惧——我永远无法从如此巨大的损失中恢复过来。在这段艰难时期,我经常和我的心理治疗师谈论所发生的事情。她看到了这场失去对我的心理健康和整体幸福感造成的巨大影响。她建议我联系 Digital Light Solution 网站https://digitallightsolution.com/,  ;从我第一次与他们的团队接触起,我就感受到了一种久违的感觉——希望。他们以专业的态度、耐心和理解的态度处理了我的案件。最重要的是,他们听取了意见。在我人生中最黑暗的时期之一,Digital Light Solution 的指导和支持帮助我重拾信心,并迈出了积极的前进步伐。今天,我分享我的故事,不仅是为了表达我的感激之情,也是为了警示他人。加密货币诈骗手段日益复杂。虚假投资平台、爱情骗局和网络求职骗局正在摧毁世界各地无辜民众的生活,榨干他们的积蓄。如果说我从这次经历中学到了什么,那就是:投资前一定要做好充分的调查研究,永远不要相信保证收益的承诺,并且要对网络保持警惕。失去辛辛苦苦挣来的钱固然令人痛苦,但提高警惕和谨慎行事可以帮助他人避免遭受同样的伤痛。电子邮件:[email protected] WhatsApp +19548568045, https://wa.link/989vlf
View full article
FlexSPI DDR/DTR mode support on LX2160A - DQS clarification needed Hello, We are working on the FlexSPI driver for the LX2160A-RDB board and have a question regarding DDR (Octal DTR) mode support. Our board has two MT35XU512ABA flash chips connected to the FlexSPI controller. We can confirm from the board schematic that the XSPI_A_DQS signal is routed from the flash (pin C3) to the LX2160A processor (pin E23). However, when we attempt to use DTR mode, flash reads return invalid data (all zeroes). SDR Octal mode (1-8-8) works correctly at various frequencies. We also noticed that in the Linux kernel, the LX2160A FlexSPI driver has FSPI_QUIRK_DISABLE_DTR set. https://lists.infradead.org/pipermail/linux-mtd/2022-July/094127.html Could you please clarify: 1. Does the LX2160A FlexSPI controller support DQS-based data sampling for DTR/DDR mode, or is this a known silicon limitation? 2. If DQS is not supported in silicon, what is the purpose of the XSPI_A_DQS pin routing on the RDB board? 3. Is there any configuration or errata that would allow DTR mode to function on LX2160A? Board: LX2160A-RDB Rev B Flash: MT35XU512ABA (*2, Octal) Reference Manual:LX2160A Reference Design Board Reference Manual, Rev. 5, 28 September 2021 Cloud Lab online debug online laboratory Virtual test Re: FlexSPI DDR/DTR mode support on LX2160A - DQS clarification needed MT35XU512ABA would have specific SPI protocol call Xccela. Not sure whether LX 2160A can support nor not Re: FlexSPI DDR/DTR mode support on LX2160A - DQS clarification needed Hello, The practical answer is: treat Octal DTR on LX2160A-RDB as unsupported in Linux/LSDK unless NXP confirms a silicon revision-specific workaround. The strongest implementation evidence is the NXP Linux patch you found: it adds FSPI_QUIRK_DISABLE_DTR for LX2160A because “lx2160a do not implement DQS,” and says this causes flash probe failure in Octal DTR mode. To your specific questions: Does LX2160A FlexSPI support DQS-based DTR/DDR sampling? The reference manual describes the FlexSPI IP as having a DQS/read-strobe sampling mode: MCR0[RXCLKSRC] = 0x3 selects “Flash provided Read strobe and input from DQS pad,” and the input timing section explicitly describes sampling with flash-provided read strobe. However, the Linux platform data for LX2160A specifically disables DTR because the platform “do[es] not implement DQS.” So I would not rely on the generic FlexSPI IP description as proof that LX2160A silicon can use external DQS for Octal DTR. Why is XSPI_A_DQS routed on LX2160A-RDB? The DQS pin is not only a flash-provided read strobe. The manual describes A_DQS as an I/O with multiple possible functions: external read strobe, latency information, and loopback dummy read strobe; it also notes that board-level loading on this pin can be used to compensate DATA/SCLK loading in loopback mode. The same FlexSPI block also uses DQS/RWDS as a write-mask-related signal for some write operations. Therefore, the RDB routing is consistent with the FlexSPI pin/function set and board compatibility, but it does not by itself prove that LX2160A supports external DQS-based Octal DTR reads. Is there any configuration or errata that enables DTR on LX2160A? I found the documented configuration for DQS mode — MCR0[RXCLKSRC] = 0x3 , with DLL settings such as SLVDLYTARGET=0xF , DLLEN=1 , OVRDEN=0 when using flash-provided read strobe; for serial root clocks below 100 MHz, the manual says to use DLL override mode with OVRDEN=1 and tune OVRDVAL , with N = 18 given as a recommended value that may need adjustment. But the LX2160A-specific Linux quirk says DTR is disabled because DQS is not implemented on LX2160A, and I did not find an LX2160A erratum or documented workaround that re-enables DQS/DTR after checking the LX2160A reference manual/datasheet material, RDB reference manual material, NXP/Linux patch text, and public errata-style searches https://lists.infradead.org/pipermail/linux-mtd/2022-July/094127.html Recommended position for the driver: keep FSPI_QUIRK_DISABLE_DTR for LX2160A and use SDR Octal 1-8-8 . Your symptom — SDR Octal works, DTR reads return zeroes — is consistent with the upstream decision to block DTR on this SoC rather than with a simple board routing issues. Regards
View full article
How to Recover Your Lost Bitcoin Without Falling Victim to Another Scam I never imagined I would become a victim of a cryptocurrency investment scam. Like many others, I was promised high returns and convinced that my investment was safe. What started as a promising cryptocurrency investment quickly turned into one of the most painful experiences I have ever faced. Like many people searching for financial growth and security, I trusted what appeared to be a legitimate investment platform. The website looked professional, the representatives were convincing, and genuine. Over time, I invested a total of €210,000 in Bitcoin, believing I was building a better future for myself and my family. Then, without warning, everything changed. When I tried to withdraw my funds, I encountered delays, excuses, and requests for additional payments. Soon after, communication stopped completely. It became painfully clear that I had fallen victim to a sophisticated scam. The emotional impact was overwhelming. I felt betrayed, embarrassed, and devastated. The money I had worked so hard to earn was gone, and with it went my confidence and peace of mind, countless moments of self-blame, and a growing fear that I would never recover from such a significant loss. During this difficult period, I regularly spoke with my therapist about what had happened. She saw how much the loss was affecting my mental health and overall well-being. she suggested that I reach out to Digital Light Solution Website https://digitallightsolution.com/, ; From my first interaction with their team, I felt something I had not felt in a long time—hope. They treated my case with professionalism, patience, and understanding. Most importantly, they listened. During one of the darkest periods of my life, Digital Light Solution their guidance and support helped me regain confidence and take positive steps forward. Today, I share my story not only to express my gratitude but also to warn others. Cryptocurrency scams are becoming more sophisticated every day. Fake investment platforms, romance scams, and online job scams are destroying lives and draining the savings of innocent people around the world. If there is one lesson I learned from this experience, it is this: always do thorough research before investing, never trust promises of guaranteed returns, and remain vigilant online. Losing your hard-earned money can be devastating, but awareness and caution can help protect others from experiencing the same heartbreak. Email:[email protected] WhatsApp +19548568045, https://wa.link/989vlf
View full article
iMX8M Plus - SW1 ON/OFF Button Hi, We are working on the iMX8M Plus EVK,In that we observed that holding SW1 for about 5 seconds powers off the EVK, and pressing it for about 1 second powers it on again. Please confirm whether this behavior is handled by hardware/PMIC or by software. Also, when SW3 is moved to the ON position, the board powers on automatically without pressing SW1. Please confirm whether this is the expected default behavior of the i.MX8M Plus EVK. Re: iMX8M Plus - SW1 ON/OFF Button Hi @Govind1807, Thank you for contacting NXP Support. This behavior is related to an internal FSM implemented within the processor.  For a better understanding, I have attached the corresponding block diagram that illustrates the FSM behavior and its state transitions. Best regards, Chavira
View full article
External JTAG debugger connection on FRDM-i.MX95 does not output expected JTAG signals Hello, I am trying to connect an external JTAG debugger to the FRDM-i.MX95 board. According to the board schematic, the JTAG/DAP signals appear to be routed to test points on the PCB, and some related components are marked as DNP. Based on this, I modified the board as follows: Connected the JTAG signals from the test points Mounted the DNP resistors related to the JTAG/DAP signal path Added a connector for an external debugger Connected VTref, GND, TCK, TMS, TDI, TDO, and RESET to the external debugger However, I cannot observe the expected JTAG signal output from the debugger/board side. For example, TCK/TMS/TDI do not appear as expected during the debugger connection sequence. Could you please confirm the following points? Is the above modification method correct for connecting an external JTAG debugger to the FRDM-i.MX95 board? Are there any additional resistors, jumpers, solder bridges, or board modifications required to enable the external JTAG/DAP interface? Is there any requirement for VTref voltage level or power sequencing before the external debugger starts driving JTAG signals? Does the i.MX95 on FRDM-i.MX95 require any boot mode, fuse setting, security setting, or software initialization before the JTAG/DAP interface becomes accessible? Can the external JTAG debugger access the Cortex-A55, Cortex-M33, and Cortex-M7 cores directly on this board, or is additional initialization by the bootloader/firmware required? Is there any recommended connector pin assignment or reference modification guide for using an external debugger with FRDM-i.MX95? I would appreciate it if you could provide any guidance, schematic references, or required modification details for enabling external JTAG debugging on the FRDM-i.MX95 board. Best regards, Re: External JTAG debugger connection on FRDM-i.MX95 does not output expected JTAG signals 1. Is your modification approach correct? In principle, yes. If the FRDM schematic exposes: TCK TMS TDI TDO nTRST or RESET VTref GND through test points and DNP stuffing options, then routing those signals to a connector is generally the correct approach. However, I cannot confirm that all required DNP resistors have been populated because the schematic itself was not returned by the search results. The user manual does not contain the JTAG circuitry. 2. Why would no TCK/TMS/TDI activity be seen? Normally, when a JTAG probe is connected: TCK/TMS/TDI are driven by the debugger. The target board does not generate them. If you see absolutely no toggling on TCK/TMS: Most common cause #1: VTref not detected Many probes (Lauterbach, J-Link, PE Micro, ULINK, etc.) will not drive JTAG pins until VTref is present and within a valid range. Check: VTref voltage at the connector. Common ground connection. Probe software reports the target voltage. For FRDM-i.MX95, the DAP I/O supply appears related to the 3.3 V domain (NVCC_CCM_DAP). The board documentation shows this domain powered from VDD_3V3. Most common cause #2: Board not powered Most debuggers use VTref for sensing only. They do not power the target. Verify: Board powered from J25. PMIC started. VDD_3V3 present. Board LEDs active. The board requires external PD power. Most common cause #3: Missing signal routing rework If the JTAG path contains: 0-Ω DNP resistors isolation resistors alternative stuffing options then missing even a single resistor can leave TCK/TMS disconnected. Since the schematic is not available in the search results, I cannot verify the exact resistor population list. Most common cause #4: Wrong pin mapping Verify with an ohmmeter: Probe pin → connector pin → resistor → test point → i.MX95 ball. Do not assume the test point labels match standard ARM 20-pin ordering. 3. Is a special boot mode required? For a non-secure device: No boot mode should be required just to observe JTAG clock activity. TCK/TMS should toggle as soon as the debugger detects VTref and starts a scan sequence. The boot switches affect: eMMC boot SD boot serial downloader and are unrelated to whether the debugger generates TCK. 4. Are security settings/fuses involved? Potentially. The i.MX95 implements authenticated debug and debug access control. [i.MX95RM_Rev4 | PDF], [i.MX95RM_Rev2 | PDF], [i.MX95 Sec...2026-final | PowerPoint] However: Security settings would usually prevent successful debug access. They would not normally prevent the debugger from generating TCK/TMS itself. Since you report no TCK activity at all, I would first investigate: VTref Probe configuration Cable pinout Missing population options before suspecting security. 5. Can A55, M33, and M7 be debugged? The i.MX95 debug architecture supports: Cortex-A55 Cortex-M33 Cortex-M7 through the CoreSight/DAP infrastructure. [i.MX95RM_Rev2 | PDF], [i.MX95RM_Rev5 | PDF] So from a silicon capability perspective, yes. Whether all domains are immediately visible depends on: system state, security configuration, debugger support. But no additional bootloader initialization is generally required for the debugger to detect the DAP itself. Recommended measurements Before further board rework, I would check: Power VTref = ? V VDD_3V3 present Board booting normally Continuity TCK connector ↔ SoC path TMS connector ↔ SoC path TDI connector ↔ SoC path TDO connector ↔ SoC path RESET connector ↔ SoC path Probe side Does the debugger software report target voltage? Does it show "target detected"? Does it report JTAG chain scan attempted? Oscilloscope Probe directly at: debugger connector pin SoC-side test point during connect attempt. If TCK is present at the debugger connector but absent at the SoC test point, the issue is almost certainly in the board rework. Re: External JTAG debugger connection on FRDM-i.MX95 does not output expected JTAG signals Thank you for your support. We reviewed our external JTAG debugger connection and found that the issue was caused by the wiring length between the FRDM-i.MX95 board and the external JTAG debugger. After shortening and rearranging the JTAG signal wires, the debugger was able to detect the target correctly and the JTAG signals were observed as expected. Therefore, this issue has been resolved by improving the JTAG wiring length and connection quality. Thank you again for your assistance.
View full article
USB OUTトランザクションでACKが欠落しています 私のチームは、USB OUTトランザクションでACKが欠落するという問題に直面しています。 当システムに関する情報: * MCUはLPC5528 * SDK バージョンは 26.03.00 です。 * Call to USB_DeviceInitでは、最初のパラメータ(controllerId)としてkUSB_ControllerLpcIp3511Fs0を提供しているので、USBフルスピードを使用しています。 パターンについて多くを語るのは難しい。私たちがCANのは次の通りです: * USB経由で大量のメッセージを送信する場合、まれにOUTトランザクションでACKが欠落することがあります。Ellisys USBアナライザーでこれを検出しました。抜けたものが見え、その後PCから3回の再試行、そしてUSBリセットが確認できます。 * それはめったに起こらない。同じ単純なUSBメッセージを繰り返し送信するスクリプトを設定しました(ターゲットは単にデータを返すだけで、複雑な計算などは行いません)。エラーが発生するまでに、数回の反復処理で済む場合もあれば、数千回の反復処理が必要な場合もある。 これが既知の問題なのか、あるいはデバッグのための何らかのコツがあるのかを知りたいです。 Re: Missing ACK on USB OUT Transactions こんにちは、 @JacobBerggreenさん LPC55S2x/LPC552xのエラータを確認しましたが、USB0フルスピードデバイス出力に直接対応するACKの欠如に関する既知の問題は見つかりませんでした。現在、USBの訂正表は主に高速モードに焦点を当てているため、あなたの構成に直接適用できるわけではありません。 この現象から考えられるより可能性の高い理由は、OUTエンドポイントが特定のタイミングで受信バッファを適時に準備しなかったため、ホストがOUTを送信した際にデバイスがACKに応答できず、再試行やリセットがトリガーされたということである。各アウトが完了した直後にUSB_SeviceRecvRequest()が呼び出されるかどうかを確認し、コールバックのプロセッシングを最小限に抑えることが推奨されます。USB割り込みの優先順位を確認し、長時間のシャットダウン割り込みを避けることも推奨されます。 BR ハリー
View full article
工业堆栈支撑 我们计划启动一个涉及多种工业协议的项目。 以下是我的问题。 NXP是否为其MCU和MPU平台提供工业通信协议栈?这些功能仅限于 i.MX94 和 i.MX-RT1180 吗?  NXP目前支持哪些工业通信协议? PROFINET EtherNet/IP EtherCAT Modbus TCP/RTU OPC UA TSN PROFIsafe CIP 功能安全 IO-Link HART-IP 其他 哪些 NXP 硬件平台支持这些协议栈? i.MX系列 S32系列 MCX系列 LPC系列 其他平台 是否有平台与协议支持矩阵? 协议栈是否提供示例应用程序、参考设计和演示项目? 是否有Linux和RTOS集成的示例? 工业协议栈的许可模式是什么? 协议栈是否免费提供?如果是,资格标准和使用条件是什么? 对评估、开发或商业部署是否有任何限制? 协议栈以何种形式提供? 二进制库 目标代码 源代码 SDK 包 是否可以访问协议栈的源代码? 如果源代码可用,获取源代码需要满足哪些商业、许可或保密协议要求? 协议栈是否可以由客户进行定制和修改? 使用 NXP 协议栈实现产品商业化的流程是什么? 商业产品部署是否涉及一次性许可费用? 是否有任何按设备计费的版税、经常性费用或年度维护费? 与评估用途相比,生产部署是否存在任何额外成本? Re: Industrial stack support 你好, 1. PROFINET - 支持。 EtherNet/IP - 支持。 EtherCAT - 支持。 Modbus TCP/RTU - 支持。 OPC UA - 支持。 TSN - 支持。 PROFIsafe - 不支持。 CIP 功能安全 - 已支持 IO-Link - 支持。 HART-IP - 不支持。 2. 这些家庭都支持前面提到的一些协议,但并非同时支持所有协议。正如您所提到的,i.MX94 和 i.MX-RT1180 都专注于支持这些协议。您也可以看看 Layerscape 处理器。 3. 不,我们没有这样的资源。 4. 是的,我们的 BSP/SDK 中有示例。 5. 是的,有例子可供参考。 6. 7. 8.这取决于提供给客户的方式,需要检查每项资源以确认许可模式。 9. 提供源代码和 SDK 包。 10. 提供源代码。 11.这取决于提供给客户的方式,需要检查每项资源以确认许可模式。 12. 可由客户修改。 13.这取决于提供给客户的方式,需要检查每项资源以确认许可模式。 14. 15. 16.NXP 无法就何时、何地以及如何获得许可提供法律指导,因为这些许可是由第三方提供的,条款各不相同(有时还会变化)。 我建议您联系您希望使用的特定协议的所有者,以获取有关版税的信息。 顺祝商祺!
View full article
Missing ACK on USB OUT Transactions My team is having some issues with missing ACKs on USB OUT transactions. Some info on our system: * The MCU is LPC5528 * SDK version is 26.03.00. * For call to USB_DeviceInit, we supply kUSB_ControllerLpcIp3511Fs0 as the first parameter (controllerId) so we're using USB full speed. It's hard to say much about patterns. What we can state is: * When we send a lot of messages over USB, once in a while an OUT transaction is missing the ACK. We've caught this with an Ellisys USB analyser. We can see the missing OUT, then 3 retries from the PC and then a USB reset. * It happens rarely. We set up a script repeating the same simple USB message (target just returns some data, no heavy computing etc.). Sometimes it takes a few iterations, other times thousands of iterations, before the error happens. We'd like to know if this is a known issue or perhaps there are some tricks to debugging it. Re: Missing ACK on USB OUT Transactions Hi @JacobBerggreen  We have checked the  errata of LPC55S2x/LPC552x and have not found any known issues with the lack of ACK directy corresponding to USB0 full speed device OUT. Currently, USB errata mainly focuses on high-speed mode, so it is not directly applicable to your configuration. From the phenomenon, the more likely reason is that the OUT endpoint did not prepare the receiving buffer in a timely manner at certain moments, resulting in the device being unable to respond to ACK when the host sends OUT, triggering retry or even reset. It is recommended to focus on confirming whether USB_SeviceRecvRequest() is immediately called after each OUT is completed, and try to minimize the processing in the callback. It is also recommended to check the priority of USB interrupts, avoid long shutdown interrupts. BR Harry
View full article
nfclibを使ってInfineon Mifare Classicを読み込む こんにちは、 私の製品 では、PN5190とNFC Libを使って 様々な種類のカードを読み取っています。ある お客様 で 問題 が発生し ています。 デバイス は オリジナル の MIFARE Classic カード を 問題 なく 読み込む のですが、 その お客様は すでに NXP チップ と インフィニオン チップ を 使ったカードを混用しています。 The NXP cards CAN be read just fine.しかし、インフィニオン製カードの場合、デバイスは認証を行うことができません。私は簡略化されたAPIデモをベースに使用していますが、これらのカードは「 ATQAが統合されたタイプAレイヤー3カード」として検出されます。ATQA は 0x0400 、 SAK は 0x88 です が 、 NXP チップ では SAK が 0x08 と 表示されます 。 まず、 MIFARE Classicで使っている のと同じコードを実行しようとしました が、 認証が失敗しました。PeerInfo.uTi.uInitiator.tIso14443_3a.bSakのSAKを変更すると、私も同じ結果になります。おそらく、実際のデータはリーダーに保存されており、ピア情報は「双方向」ではない。例を確認しましたが、この特定の状況に関する情報はありませんでした。互換性のあるカードの読み取り方法に関する情報はありますか? スマホ でカード をCAN読み取 れて問題なく動作 します(元のNXPカードより遅いかもしれませんが、動作します)。 セクター0のダンプは以下のとおりです。 XXXXXXXXC188040043242BCE0001020E XXXXXXXXXXXXXXXX0000000000000000 FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF XXXXXXXXXXXXFF078069XXXXXXXXXXXX NFCライブラリは、以下のエラーコードを返します。 エラー情報 Comp: 0x0 タイプ: 0x0 の 結果 の 送信中 の 認証する 指示 は 0x20000 。 何か例はありますか? 前もって感謝します。 Re: Reading infineon mifare classic using nfclib こんにちは、 @Saydev さん。 あなたの調子が良いといいのですが。 レイヤ3は衝突防止、UID選択、カードのアクティベーションをカバーし、ISO 14443のレイヤ4はデータ交換のための標準化されたコマンドのセットを提供します。基本的なタグ/カードはレイヤー3で処理を停止し、レイヤー4の代わりに独自のメモリ読み書きコマンドを使用します。 お客様がサードパーティのPICC(中身)を使っている場合、デバイス向けに独自のカスタムコマンドセットを実装する必要があります。 また、NxpNfcRdlib -> types -> ph_Status.h も参照してください。ステータスコードの定義については、こちらをご覧ください。 よろしくお願いいたします。 エドゥアルド。 Re: Reading infineon mifare classic using nfclib こんにちは、エドゥアルドさん。 このカードはスマホアプリでMIFARE Classic 1kとして認識され、適切なキーを読み込めば問題なく読み取れます(専用ソフトウェアは不要で、Android用のMIFARE Classicツールだけで済みます)。したがって、このカードは標準的なコマンドを受け付けていると思います(チップのモデルはまだ調べていませんが、ファミリのSLE 78CLXxxxPの一つだと思います)。 データシートには「MIFARE™ 互換インターフェース」と書かれていますが、互換性はエミュレートされているかもしれませんが、動作します。nfclibに付属していた例コードを確認しましたが、ATQAは0x0400、SAKは0x08と期待されています。問題はSAK値が予想値と異なることに関係していると思います。読者にSAKが0x08だと信じ込ませる方法はありますか? Re: Reading infineon mifare classic using nfclib 良いニュースです、 カードの読み取りはできました。カードの読み取り方法を簡略化されたAPIからNfcrdlibEx4_MIFAREClassic.cに示されている方法に変更しただけです。例えば、マクロ phalMfc_Authenticate はこれらのカードで問題なく動作するようですが、MFC_AUTHENTICATE は失敗していました。
View full article
Reading infineon mifare classic using nfclib Hi, In my product, I use the PN5190 with NFC Lib to read different types of cards. I’m having an issue with one customer: the device reads original MIFARE Classic cards without problems, but this customer has already deployed a mix of cards using NXP chips and Infineon chips. The NXP cards can be read just fine. However, with the Infineon cards, the device is unable to authenticate. I’m using as a base the simplified API demo, and these cards are detected as: “Type A Layer 3 card with merged ATQA”. The ATQA is 0x0400 and the SAK is 0x88, but on the NXP chip the SAK shows 0x08. First, I tried running the same code that I use for MIFARE Classic, but authentication fails. If I modify the SAK in PeerInfo.uTi.uInitiator.tIso14443_3a.bSak, I get the same result. Likely, the real data is kept in the reader and the peer info isn’t “bidirectional.” I’ve checked the examples, but there’s no information for this specific situation. Any info on how to read compatible cards? I can read the card with my phone and it works fine (maybe slower than an original NXP card, but it works). The sector 0 dump is: XXXXXXXXC188040043242BCE0001020E XXXXXXXXXXXXXXXX0000000000000000 FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF XXXXXXXXXXXXFF078069XXXXXXXXXXXX NFC Lib returns this error code: ErrorInfo Comp: 0x0 type: 0x0 The result of sending the authenticate command is 0x20000. Any example? Thanks in advance. Re: Reading infineon mifare classic using nfclib Hello @Saydev Hope you are doing well. Layer 3 covers anti-collision, UID selection and card activation, while ISO 14443 layer 4 presents a set of standardized commands for data exchange. Basic Tags/Cards stop after Layer 3 and use proprietary memory-read/write commands instead of Layer 4. Since your customer is using third-party PICCs, you will need to implement the proprietary/custom command set for your device. Also, please refer to NxpNfcRdlib -> types -> ph_Status.h for the Status Code definitions. Regards, Eduardo. Re: Reading infineon mifare classic using nfclib Good news, I've been able to read the card, i simply changed the way to read the card from simplified API to the approach shown in the NfcrdlibEx4_MIFAREClassic.c example, the macro phalMfc_Authenticate seems to work just fine with these cards while MFC_AUTHENTICATE was failing. Re: Reading infineon mifare classic using nfclib Hi Eduardo, The card is detected by the phone app as mifare classic 1k and it can be read just fine once the proper keys are loaded (no proprietary software is needed, just mifare classic tool for android), therefore i think the card accepts standard commands (i still need to discover the chip model, but i think it's one of the family SLE 78CLXxxxP, on the datasheet it says to have " Mifare™ compatible interface"), maybe the compatibility is emulated but it works, I've checked the example code that came with nfclib and it expects to have a ATQA of 0x0400 and SAK of 0x08, i think that the problem is related to the SAK value having a different value than expected. is there any way to force the reader to believe the SAK is 0x08?
View full article
使用 nfclib 读取英飞凌 Mifare Classic 卡 您好, 在我的产品中,我使用PN5190和NFC Lib来读取不同类型的卡片。我遇到一个客户的问题:该设备可以毫无问题地读取原装MIFARE Classic卡,但这位客户已经部署了使用NXP芯片和Infineon芯片的混合卡。 NXP卡可以正常读取。​​但是,使用英飞凌卡时,该设备无法进行身份验证。我以简化的API演示为基础,这些卡片被检测为: “带有合并ATQA的A类3层卡” 。ATQA 为 0x0400 , SAK 为 0x88 , 但 在 NXP 芯片 上 , SAK 显示为 0x08 。 首先,我尝试运行与MIFARE Classic相同的代码,但身份验证失败。如果我修改PeerInfo.uTi.uInitiator.tIso14443_3a.bSak中的SAK ,我得到的结果也一样。很可能,真实数据保存在阅读器中,而同伴信息不是“双向的” 。我查阅了示例,但没有找到针对这种情况的信息。有关于如何读取兼容存储卡的信息吗? 我可以用手机读取这张卡,而且读取效果很好(可能比原装NXP卡慢一些,但能用) 。0 区转储内容为: XXXXXXXXC188040043242BCE0001020E XXXXXXXXXXXXXXXX0000000000000000 FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF XXXXXXXXXXXXFF078069XXXXXXXXXXXX NFC Lib返回此错误代码: ErrorInfo Comp: 0x0 type: 0x0 这 结果 的 发送 这 认证 命令 是 0x20000 。 有例子吗? 提前致谢。 Re: Reading infineon mifare classic using nfclib 你好@Saydev 希望你一切都好。 第 3 层涵盖防碰撞、UID 选择和卡激活,而 ISO 14443 第 4 层提供了一组用于数据交换的标准化命令。基本标签/卡片在第 3 层之后停止,并使用专有的内存读取命令和写入命令,而不是第 4 层。 由于您的客户使用的是第三方 PICC,您需要为您的设备实现专有/自定义命令集。 另外,请参阅 NxpNfcRdlib -> types -> ph_Status.h用于状态码定义。 问候, 爱德华多。 Re: Reading infineon mifare classic using nfclib 好消息, 我已经能够读取这张卡了,我只是把读取卡片的方式从简化的 API 改成了 NfcrdlibEx4_MIFAREClassic.c 文件中所示的方法。例如,宏 phalMfc_Authenticate 似乎可以很好地处理这些卡,而 MFC_AUTHENTICATE 却失败了。 Re: Reading infineon mifare classic using nfclib 你好,爱德华多, 手机应用能识别出这张卡是 Mifare Classic 1k,加载正确的密钥后也能正常读取(无需任何专用软件,只需安卓版的 Mifare Classic 工具即可)。因此,我认为这张卡可以接受标准命令(我还需要查一下芯片型号,但我认为它是 SLE 78CLXxxxP 系列的其中一款,数据手册上写着“兼容 Mifare ™接口”)。也许这种兼容性是模拟的,但它确实有效。我查看了 nfclib 自带的示例代码,它预期 ATQA 值为 0x0400,SAK 值为 0x08。我认为问题出在 SAK 值与预期值不同上。有没有办法让读者相信 SAK 是 0x08?
View full article
FRDM-i.MX95 上的外部 JTAG 调试器连接未输出预期的 JTAG 信号 你好, 我正在尝试将外部 JTAG 调试器连接到 FRDM-i.MX95 板。 根据板原理图,JTAG/DAP 信号似乎被连接到 PCB 上的测试点,一些相关元器件被标记为 DNP。 基于此,我对电路板进行了如下修改: 连接测试点的 JTAG 信号 安装与 JTAG/DAP 信号路径相关的 DNP 电阻器 添加了外部调试器的连接器 将 VTref、GND、TCK、TMS、TDI、TDO 和 RESET 连接到外部调试器 但是,我无法从调试器/电路板端观察到预期的 JTAG 信号输出。 例如,在调试器连接序列期间,TCK/TMS/TDI 没有按预期出现。 请您确认以下几点? 上述修改方法是否适用于将外部 JTAG 调试器连接到 FRDM-i.MX95 板? 要启用外部 JTAG/DAP 接口,是否需要额外的电阻器、跳线、焊桥或板修改? 外部调试器开始驱动 JTAG 信号之前,VTref 电压等级或电源时序是否有任何要求? FRDM-i.MX95 上的 i.MX95 在 JTAG/DAP 接口可访问之前是否需要任何启动模式、熔丝设置、网络安全设置或软件初始化? 外部 JTAG 调试器能否直接访问该板上的 Cortex-A55、Cortex-M33 和 Cortex-M7 内核,还是需要引导加载程序/固件进行额外的初始化? 在使用 FRDM-i.MX95 时,是否有推荐的连接器引脚分配或参考修改指南,以便将外部调试器与 FRDM-i.MX95 配合使用? 如果您能提供在 FRDM-i.MX95 板上启用外部 JTAG 调试的任何指导、原理图参考或所需修改细节,我将不胜感激。 顺祝商祺! Re: External JTAG debugger connection on FRDM-i.MX95 does not output expected JTAG signals 1. 你的修改方法是否正确? 原则上,是的。 如果 FRDM 原理图显示: TCK TMS TDI TDO nTRST 或 RESET VTREF GND 通过测试点和 DNP 填充选项,然后将这些信号路由到连接器通常是正确的方法。 但是,由于搜索结果中没有返回原理图,因此我无法确认所有必需的 DNP 电阻器是否都已安装到位。用户手册中不包含 JTAG 电路图。 2. 为什么检测不到 TCK/TMS/TDI 活性? 通常情况下,当连接 JTAG 探针时: TCK/TMS/TDI 由调试器驱动。 目标板不会生成它们。 如果您在 TCK/TMS 上完全看不到任何切换: 最常见原因 1:未检测到 VTref 许多探针(Lauterbach、J-Link、PE Micro、ULINK 等)只有在 VTref 存在且在有效范围内时才会驱动 JTAG 引脚。 检查: 连接器处的 VTref 电压。 共用接地连接。 探针软件会报告目标电压。 对于 FRDM-i.MX95,DAP I/O 电源似乎与 3.3 V 功能域 (NVCC_CCM_DAP) 有关。板文档显示该功能域由VDD_3V3供电。 最常见原因二:电路板未通电 大多数调试器仅使用 VTref 进行检测。 它们不会为目标提供动力。 核实: 电路板由 J25 供电。 PMIC启动。 VDD_3V3 存在。 电路板上的LED指示灯亮起。 该板需要外部PD电源。 最常见原因#3:缺少信号路由重构 如果 JTAG 路径包含: 0Ω DNP电阻器 隔离电阻器 其他馅料选择 即使缺少一个电阻,也可能导致 TCK/TMS 断开连接。 由于搜索结果中没有原理图,我无法核实电阻器的确切配置。 最常见原因#4:引脚映射错误 用欧姆表验证: 探针引脚 → 连接器引脚 → 电阻器 → 测试点 → i.MX95 球。 不要假设测试点标签与标准的 ARM 20 引脚顺序一致。 3. 是否需要特殊的启动模式? 对于不安全的设备: 观察 JTAG 时钟活动不应该需要启动模式。 一旦调试器检测到 VTref 并开始扫描序列,TCK/TMS 就应该切换。 启动开关会影响: eMMC启动 SD启动 序列号下载器 这与调试器是否生成 TCK 无关。 4. 是否涉及安全设置/熔丝? 有可能。 i.MX95 实现了认证调试和调试访问控制。[i.MX95RM_Rev4 | PDF] 、 [i.MX95RM_Rev2 | PDF] 、 [i.MX95 Sec...2026-final | PowerPoint] 然而: 网络安全设置通常会阻止成功的调试访问。 它们通常不会阻止调试器生成 TCK/TMS 本身。 由于您报告完全没有 TCK 活性,我首先会调查以下问题: VTREF 探针配置 电缆引脚排列 缺失的人口选项 在怀疑网络安全之前。 5. A55、M33 和 M7 可以调试吗? i.MX95调试架构支持: Cortex-A55 Cortex-M33 Cortex-M7 通过 CoreSight/DAP 基础设施。[i.MX95RM_Rev2 | PDF] , [i.MX95RM_Rev5 | PDF] 所以从硅芯片的性能角度来看,是的。 所有功能域是否立即可见取决于: 系统状态, 网络安全配置, 支持调试器。 但调试器通常不需要额外的引导加载程序初始化即可检测到 DAP 本身。 推荐测量方法 在进一步修改电路板之前,我会检查以下几点: 电源 VTref = ?V VDD_3V3 存在 板正常启动 连续性 TCK 连接器 ↔ SoC 路径 TMS连接器↔SoC路径 TDI 连接器 ↔ SoC 路径 TDO 连接器 ↔ SoC 路径 RESET 连接器 ↔ SoC 路径 探针侧 调试软件是否报告目标电压? 它是否显示“检测到目标”? 它是否报告尝试进行 JTAG 链扫描? 示波器 直接探测: 调试器连接器引脚 SoC侧测试点 连接尝试期间。 如果调试器连接器处存在 TCK,但 SoC 测试点处不存在 TCK,则问题几乎肯定出在电路板返工上。 Re: External JTAG debugger connection on FRDM-i.MX95 does not output expected JTAG signals 感谢您的支持。 我们检查了外部 JTAG 调试器连接,发现 问题是由FRDM-i.MX95板和电路板之间的线路长度引起的。 外部 JTAG 调试器。 缩短并重新排列 JTAG 信号线后,调试器…… 能够正确检测到目标,并观察到了JTAG信号。 预期的。 因此,通过改进JTAG接线方式,这个问题已经得到解决。 长度和连接质量。 再次感谢您的帮助。
View full article
USB 输出事务缺少 ACK 我的团队在 USB 输出事务中遇到了 ACK 缺失的问题。 关于我们系统的一些信息: * MCU 型号为 LPC5528 * SDK 版本为 26.03.00。 * 对于 USB_DeviceInit 的调用,我们将 kUSB_ControllerLpcIp3511Fs0 作为第一个参数(controllerId)提供,以便我们使用 USB 全速。 很难对模式做出太多评价。我们可以肯定的是: * 当我们通过 USB 发送大量消息时,偶尔会出现 OUT 事务缺少 ACK 的情况。我们用Ellisys USB分析仪检测到了这个问题。我们可以看到缺少 OUT 信号,然后 PC 进行了 3 次重试,最后通过 USB RESET。 这种情况很少发生。我们编写了一个脚本,重复发送相同的简单 USB 消息(目标只是返回一些数据,没有繁重的计算等)。有时只需几次迭代,有时则需要数千次迭代才会出现错误。 我们想知道这是否是一个已知问题,或者是否有调试技巧。 Re: Missing ACK on USB OUT Transactions 嗨@JacobBerggreen 我们已经检查了 LPC55S2x/LPC552x 的勘误表,没有发现任何与 USB0 全速设备输出直接对应的缺少 ACK 相关的已知问题。目前,USB勘误表主要集中在高速模式上,因此并不直接适用于您的配置。 从这种现象来看,更可能的原因是 OUT 端点在某些时刻没有及时准备接收缓冲区,导致主机发送 OUT 时设备无法响应 ACK,从而触发信号重试甚至 RESET。建议重点确认每次 OUT 完成后是否立即调用 USB_ServiceRecvRequest(),并尽量减少回调中的处理。还建议检查 USB 中断的优先级,避免长时间的关机中断。 BR 哈里
View full article
iMX8M Plus - SW1 开/关按钮 你好, 我们正在研究 iMX8M Plus EVK,我们发现按住 SW1 约 5 秒钟会关闭 EVK,而按住 SW1 约 1 秒钟会再次打开 EVK。请确认此行为是由硬件/电源管理集成电路 (PMIC) 还是软件处理的。 另外,当 SW3 移到 ON 位置时,板会自动通电,无需按下 SW1。请确认这是否是 i.MX8M Plus EVK 的预期默认行为。 Re: iMX8M Plus - SW1 ON/OFF Button 你好@Govind1807 , 感谢您联系恩智浦技术支持。 这种行为与处理器内部实现的有限状态机有关。 为了更好地理解,我附上了相应的框图,该框图说明了有限状态机的行为及其状态转换。 此致, 查维拉
View full article
Industrial stack support We are planning to start a project that will have multiple Industrial protocol. Below are my queries. Does NXP provide industrial communication protocol stacks for its MCU and MPU platforms? Is these limited to i.MX94 & i.MX-RT1180?  Which industrial communication protocols are currently supported by NXP? PROFINET EtherNet/IP EtherCAT Modbus TCP/RTU OPC UA TSN PROFIsafe CIP Safety IO-Link HART-IP Others  Which NXP hardware platforms support these protocol stacks? i.MX series S32 series MCX series LPC series Other platforms  Is there a platform-versus-protocol support matrix available?  Are sample applications, reference designs, and demonstration projects provided with the protocol stacks?  Are Linux and RTOS integration examples available?  What is the licensing model for the industrial protocol stacks?  Are the protocol stacks available free of charge? If yes, what are the eligibility criteria and usage conditions?  Are there any restrictions on evaluation, development, or commercial deployment?  In what form are the protocol stacks provided? Binary library Object code Source code SDK package  Is source code access available for the protocol stacks?  If source code is available, what are the commercial, licensing, or NDA requirements to obtain it?  Can the protocol stacks be customized and modified by customers?  What is the process for commercializing a product using the NXP protocol stacks?  Are there any one-time licensing fees associated with commercial product deployment?  Are there any per-device royalties, recurring charges, or annual maintenance fees?  Are there any additional costs associated with production deployment versus evaluation use? Re: Industrial stack support Hello, 1. PROFINET - Supported. EtherNet/IP - Supported. EtherCAT - Supported. Modbus TCP/RTU - Supported. OPC UA - Supported. TSN - Supported. PROFIsafe - Not supported. CIP Safety - Supported IO-Link - Supported. HART-IP - Not supported. 2. All of these families support some of previous mentioned protocols but not all at the same time. As you mention i.MX94 and i.MX-RT1180 are focused to support these protocols. You can also take a look in Layerscape processors. 3. No, we do not have a resource like this. 4. Yes, there are examples in our BSPs/SDKs. 5. Yes, there are examples available. 6. 7. 8. This depends on the way that is provided to the customer and each resource needs to be checked to confirm licensing model. 9. Source code and SDK packages are available. 10. Source code is available. 11. This depends on the way that is provided to the customer and each resource needs to be checked to confirm licensing model. 12. Can be modified by customer. 13. This depends on the way that is provided to the customer and each resource needs to be checked to confirm licensing model. 14. 15. 16. NXP is legally unable to provide guidance on when, where and how to obtain licenses as these are done by 3rd parties with varying and (sometimes) changing terms. I would suggest you contact the owner of the specific protocol you wish to use for information regarding royalties. Best regards.
View full article
iMX8M Plus - SW1 電源オン/オフボタン こんにちは、 iMX8M Plus EVK の開発に取り組んでおり、SW1 を約 5 秒間押し続けると EVK の電源がオフになり、約 1 秒間押すと再び電源がオンになることを確認しました。この動作がハードウェアやPMICによって処理されるのか、それともソフトウェアによって処理されているのかを確認してください。 また、SW3をON位置に移動させると、SW1を押さずに自動的に電源が入ります。これがi.MX8M Plus EVKの想定されるデフォルト動作であるかどうかをご確認ください。 Re: iMX8M Plus - SW1 ON/OFF Button こんにちは、@Govind1807。 NXPサポートまでご連絡いただきありがとうございます。 この挙動はプロセッサ内に実装された内部FSMに関連しています。 より理解を深めていただくために、FSMの動作と状態遷移を示す対応するブロック図を添付しました。 よろしくお願いします、 チャビラ
View full article
FRDM-i.MX95の外部JTAGデバッガ接続で、期待されるJTAG信号が出力されない。 こんにちは、 FRDM-i.MX95ボードに外部JTAGデバッガを接続しようとしています。 基板の回路図によると、JTAG/DAP信号はPCB上のテストポイントに配線されているようで、関連する一部の部品はDNP(未実装)とマークされている。 これに基づき、基板を以下のように改造しました。 テストポイントからのJTAG信号をコネクテッド JTAG/DAP信号経路に関連するDNP抵抗器を取り付けました 外部デバッガ用のコネクタを追加しました VTref、GND、TCK、TMS、TDI、TDO、RESETを外部デバッガにコネクテッド しかし、デバッガやボード側からの期待されるJTAG信号の出力は観測できません。 例えば、デバッガ接続シーケンス中にTCK/TMS/TDIが期待どおりに表示されない。 以下の点を確認していただけますか? 上記の改造方法は、外部JTAGデバッガをFRDM-i.MX95ボードに接続するのに正しいのでしょうか? 外部JTAG/DAPインターフェースを有効にするために追加の抵抗、ジャンパー、はんだブリッジ、基板の改造などが必要ですか? 外部デバッガがJTAG信号の駆動を開始する前に、VTref電圧レベルや電源シーケンスに関する要件はありますか? FRDM-i.MX95上のi.MX95は、JTAG/DAPインターフェースにアクセスできるようになる前に、ブートモード、ヒューズ設定、セキュリティ設定、ソフトウェア初期化が必要ですか? 外部JTAGデバッガはこのボード上でCortex-A55、Cortex-M33、Cortex-M7コアに直接アクセスできますか?それともブートローダーやファームウェアによる追加の初期化が必要ですか? FRDM-i.MX95で外部デバッガを使用する際に推奨されるコネクタピンの割り当てや、参照変更ガイドはありますか? FRDM-i.MX95ボードで外部JTAGデバッグを有効にするためのガイダンスや回路図の参考、必要な改造の詳細を教えていただけるとありがたいです。 よろしくお願いいたします。 Re: External JTAG debugger connection on FRDM-i.MX95 does not output expected JTAG signals 1. あなたの修正方法は正しいですか? 原則的には、そうです。 FRDM回路図に以下が含まれている場合: TCK TMS TDI TDO nTRST または RESET VTref GND テストポイントやDNP(デジタルノイズプロテクタリング)オプションを通して信号を取り出し、それらの信号をコネクタにルーティングするのが、一般的に正しいアプローチです。 しかし、回路図自体が検索結果に返ってこなかったため、 必要なDNP抵抗 がすべて入力されているかは確認できません。ユーザーマニュアルにはJTAG回路は含まれていません。 2. なぜTCK/TMS/TDIの活性が見られないのでしょうか? 通常、JTAGプローブが接続されると: TCK/TMS/TDIはデバッガによって駆動されます。 ターゲットボードはそれらを生成しません。 TCK/TMSで全く切り替えが見られない場合: 最も一般的な原因その1:VTrefが検出されない 多くのプローブ(Lauterbach、J-Link、PE Micro、ULINKなど)は、VTrefが存在し、かつ有効な範囲内にあるまでJTAGピンを駆動しません。 確認: コネクタにおけるVTref電圧。 共通接地接続。 プローブソフトウェアは目標電圧を報告します。 FRDM-i.MX95の場合、DAP I/O電源は3.3Vドメイン(NVCC_CCM_DAP)に関連しているようです。ボードのドキュメントには、このドメインがVDD_3V3から電源を供給されていることが示されています。 最も一般的な原因その2:ボードに電源が供給されていない ほとんどのデバッガは、センシングのためだけにVTrefを使用します。 それらは標的に電力を供給しない。 確認する: 基板はJ25から給電されます。 PMICが起動しました。 VDD_3V3が存在します。 基板のLEDが点灯しています。 この基板には外部PD電源が必要です。 最も一般的な原因その3:信号ルーティングの再作業の不足 JTAGパスに以下が含まれる場合: 0Ω DNP抵抗器 絶縁抵抗 代替の詰め物オプション 抵抗が1つでも欠けていると、TCK/TMSが切断されることがあります。 回路図は検索結果に含まれていないため、正確な抵抗数リストを検証できません。 最も一般的な原因その4:ピンマッピングの間違い オームメーターで確認してください。 プローブピン → コネクタピン → 抵抗器 → テストポイント → i.MX95 ボール。 テストポイントラベルが標準的なARM 20ピンの順序と一致しているとは限りません。 3. 特別な起動モードが必要ですか? セキュリティ保護されていないデバイスの場合: JTAGクロックの動作を監視するだけであれば、ブートモードは必要ないはずです。 TCK/TMSは、デバッガがVTrefを検出してスキャンシーケンスを開始するとすぐに切り替わるはずです。 ブートスイッチは以下に影響します: eMMCブート SDブート シリアルダウンローダー そして、これらはデバッガがTCKを生成するかどうかとは無関係です。 4. セキュリティ設定やヒューズは関係していますか? 可能性はある。 i.MX95は認証済みデバッグおよびデバッグアクセス制御を実装しています。[i.MX95RM_Rev4 | PDF] 、 [i.MX95RM_Rev2 | PDF] 、 [i.MX95 Sec...2026-final | PowerPoint] しかし: セキュリティ設定は通常、デバッグアクセスを妨げます。 通常、それらはデバッガがTCK/TMS自体を生成することを妨げるものではありません。 TCK活性が全く見られないとの報告ですので、まずは以下を調査します。 VTref プローブ構成 ケーブルのピン配列 人口に関する選択肢が不足しています セキュリティを疑う前に。 5. A55、M33、M7はデバッグ可能か? i.MX95デバッグアーキテクチャは以下をサポートしています: コルテックス-A55 Cortex-M33 Cortex-M7 CoreSight/DAPインフラストラクチャを通じて。[i.MX95RM_Rev2 | PDF] 、 [i.MX95RM_Rev5 | PDF] シリコンの能力の観点から見ると、はい、そうです。 すべてのドメインがすぐに表示されるかどうかは、以下の要因によって決まります。 システムの状態、 セキュリティ構成、 デバッガのサポート。 しかし、デバッガがDAP自体を検出するために、通常は追加のブートローダー初期化は必要ありません。 推奨寸法 基板の再加工を行う前に、以下の点を確認します。 パワー VTref = ?V VDD_3V3 が存在する ボードは正常に起動しています 連続 TCKコネクタ ↔ SoCパス TMSコネクタ↔SoCパス TDIコネクタ↔SoCパス TDOコネクタ↔SoCパス リセットコネクタ ↔ SoCパス プローブ側 デバッガソフトはターゲット電圧を報告しますか? 「ターゲット検出」と表示されますか? JTAGチェーンスキャンが試行されたと報告されますか? オシロスコープ プローブを直接以下へ: デバッガーコネクタピン SoC側テストポイント 接続試行中。 デバッガーコネクタにTCKが存在するのに、SoCテストポイントにTCKが存在しない場合、問題はほぼ間違いなく基板の再加工にある。 Re: External JTAG debugger connection on FRDM-i.MX95 does not output expected JTAG signals 再開まで今しばらくお待ちください。 外部JTAGデバッガー接続を見直したところ、 問題は、FRDM-i.MX95 ボードと 外部JTAGデバッガ。 JTAG信号線を短くして再配置した後、デバッガは ターゲットを正しく検出することができ、JTAG信号は次のように観測された。 期待される。 そのため、この問題はJTAG配線の改良によって解決されました 長さと接続品質。 ご協力いただき、改めて感謝申し上げます。
View full article
インダストリアルスタックサポート 複数のインダストリアルプロトコルを持つプロジェクトを開始する予定です。 以下は私の質問です。 NXPはMCUおよびMPUプラットフォーム向けに産業用通信プロトコルスタックを提供していますか?これらはi.MX94とi.MX-RT1180に限定されているのでしょうか?  現在NXPがサポートしているインダストリアル通信プロトコルは? プロフィネット イーサネット/IP EtherCAT Modbus TCP/RTU OPC UA TSN プロフィセーフ CIPセーフティ IO-Link ハートイップ その他 - これらのプロトコルスタックをサポートしているNXPハードウェアプラットフォームは? i.MXシリーズ S32シリーズ MCXシリーズ LPCシリーズ その他のプラットフォーム  プラットフォームとプロトコルのサポートマトリックスは存在しますか? ‚� サンプルアプリケーション、リファレンスデザイン、デモンストレーションプロジェクトはプロトコルスタックに含まれているか? ― LinuxとRTOSの統合例はありますか?  産業用プロトコルスタックのライセンスモデルとは? ― プロトコルスタックは無料で利用可能ですか?もしそうなら、適格基準や使用条件はどのようなものですか? ・評価、開発、または商用展開に関して、何らかの制限はありますか? ― プロトコルスタックはどのような形で提供されているのか? バイナリライブラリ オブジェクトコード ソースコード SDKパッケージ ― プロトコルスタックのソースコードアクセスは可能か? ・ソースコードが入手可能な場合、それを入手するための商用、ライセンス、または秘密保持契約(NDA)に関する要件は何ですか? ― プロトコル・スタックはお客様によってカスタマイズ・修正可能か? • NXPプロトコルスタックを用いた製品の商業化プロセスはどのようなものですか? ― 商用製品の展開に伴う一度限りのライセンス料はありますか? ・デバイスごとの使用料、定期料金、または年間保守料金は発生しますか? ・本番環境への導入と評価利用では、追加費用が発生しますか? Re: Industrial stack support こんにちは、 1. PROFINET - サポート対象。 イーサネット/IP - サポート済み。 EtherCAT - 対応しています。 Modbus TCP/RTU - 対応。 OPC UA - サポートされています。 TSN - サポート中。 PROFIsafe - サポート対象外です。 CIPセーフティ - サポート済み IO-Link - サポートされています。 HART-IP - サポートされていません。 2. これらのファミリは、前述のプロトコルのいくつかをサポートしていますが、同時にすべてをサポートしているわけではありません。ご指摘の通り、i.MX94とi.MX-RT1180はこれらのプロトコルをサポートすることに重点を置いています。Layerscapeプロセッサも検討できます。 3. いいえ、そのようなリソースはございません。 4. はい、私たちのBSP/SDKsには例があります。 5. はい、例はあります。 6. 7. 8.これはお客様に提供される方法により、各リソースがライセンスモデルを確認するためにチェックする必要があります。 9. ソースコードおよびSDKsパッケージが利用可能です。 10. ソースコードが利用可能です。 11.これはお客様に提供される方法により、各リソースがライセンスモデルを確認するためにチェックする必要があります。 12. お客様によってCAN。 13.これはお客様に提供される方法により、各リソースがライセンスモデルを確認するためにチェックする必要があります。 14. 15. 16.NXPは、ライセンスの取得時期、場所、方法について法的にガイダンスを提供することはできません。ライセンスの取得は第三者によって行われ、その条件は様々であり、(場合によっては)変更されるからです。 ロイヤリティに関する情報については、使いたいプロトコルの所有者にお問い合わせいただくことをお勧めします。 よろしくお願いいたします。
View full article
LX2160A 对 FlexSPI DDR/DTR 模式的支持 - 需要 DQS 说明 你好, 我们正在开发 LX2160A-RDB 板的 FlexSPI 驱动程序,并且对 DDR(八进制 DTR)模式支持有一个疑问。 我们的板上有两个 MT35XU512ABA 闪存芯片连接到 FlexSPI 控制器。从板原理图可以确认,XSPI_A_DQS 信号从闪存(引脚 C3)路由到 LX2160A。 处理器(引脚 E23)。 但是,当我们尝试使用 DTR 模式时,闪存读取返回无效数据(全为零)。SDR八进制模式(1-8-8)在各种频率下都能正常工作。 我们还注意到,在 Linux 内核中,LX2160A FlexSPI 驱动程序设置了 FSPI_QUIRK_DISABLE_DTR。 https://lists.infradead.org/pipermail/linux-mtd/2022-July/094127.html 请问您能否澄清一下: 1. LX2160A FlexSPI 控制器是否支持 DTR/DDR 模式下的基于 DQS 的数据采样,还是这是已知的芯片限制? 2. 如果芯片不支持 DQS,那么 RDB 板上的 XSPI_A_DQS 引脚布线的目的是什么? 3. 是否有任何配置或勘误表可以让 DTR 模式在 LX2160A 上运行? 电路板:LX2160A-RDB Rev B 闪存:MT35XU512ABA(*2,八进制) 参考手册:LX2160A 参考设计板参考手册,修订版 5,2021 年 9 月 28 日 云实验室 在线调试 在线实验室 虚拟测试 Re: FlexSPI DDR/DTR mode support on LX2160A - DQS clarification needed MT35XU512ABA 将具有特定的 SPI 协议,称为 Xccela。不确定LX 2160A是否支持。 Re: FlexSPI DDR/DTR mode support on LX2160A - DQS clarification needed 你好, 实际的解决方法是:除非 NXP 确认有针对特定芯片版本的变通方案,否则 Linux/LSDK 中对 LX2160A-RDB 上的八进制 DTR 不予支持。最有力的实现证据是您找到的 NXP Linux 补丁:它为 LX2160A 添加了 FSPI_QUIRK_DISABLE_DTR 因为“lx2160a 没有实现 DQS”,并指出这会导致八进制 DTR 模式下的闪存探测失败。 针对您的具体问题: LX2160A FlexSPI 是否支持基于 DQS 的 DTR/DDR 采样? 参考手册将 FlexSPI IP 描述为具有 DQS/读取选通采样模式: MCR0[RXCLKSRC] = 0x3 选择“闪存提供的读取选通和来自 DQS 焊盘的输入”,并且输入时序部分明确描述了使用闪存提供的读取选通进行采样。然而,LX2160A 的 Linux 平台数据明确禁用了 DTR,因为该平台“不实现 DQS”。因此,我不会依赖通用的 FlexSPI IP 描述来证明 LX2160A 芯片可以使用外部 DQS 进行八进制 DTR。 为什么 XSPI_A_DQS 被路由到 LX2160A-RDB? DQS 引脚不仅仅是闪光灯提供的读取频闪信号。该手册将 A_DQS 描述为具有多种可能功能的 I/O:外部读取选通、延迟信息和环回虚拟读取选通;它还指出,可以在此引脚上进行板级加载,以补偿环回模式下的 DATA/SCLK 加载。同一个 FlexSPI 模块还使用 DQS/RWDS 作为某些写入操作的写掩码相关信号。因此,RDB 布线与 FlexSPI 引脚/功能集和板兼容性一致,但这本身并不能证明 LX2160A 支持基于外部 DQS 的八进制 DTR 读取。 LX2160A 是否有任何配置或勘误表可以启用 DTR? 我找到了 DQS 模式的文档配置 MCR0[RXCLKSRC] = 0x3 ,当使用闪存提供的读取选通时,DLL 设置如下: SLVDLYTARGET=0xF , DLLEN=1 , OVRDEN=0 ;对于低于 100 MHz 的串行根时钟,手册建议使用 DLL 覆盖模式, OVRDEN=1 ,并调整 OVRDVAL ,其中 N = 18 是一个推荐值,可能需要调整。但LX2160A特有的Linux问题指出,由于LX2160A未实现DQS,因此DTR功能被禁用。我查阅了LX2160A参考手册/数据手册、RDB参考手册、NXP/Linux补丁文本以及公开的勘误表,均未找到任何关于重新启用DQS/DTR的LX2160A勘误或已记录的解决方法。 https://lists.infradead.org/pipermail/linux-mtd/2022-July/094127.html 推荐的驱动程序位置:对 LX2160A 保持 FSPI_QUIRK_DISABLE_DTR ,并使用 SDR 八进制 1-8-8 。您的症状——SDR 八进制工作,DTR 读取返回零——与上游决定阻止此 SoC 上的 DTR 一致,而不是简单的板布线问题。 此致
View full article
LX2160AにおけるFlexSPI DDR/DTRモードのサポート - DQSの説明が必要です こんにちは、 私たちはLX2160A-RDBボード用のFlexSPIドライバを開発中で、DDR(オクタルDTR)モードのサポートについて質問があります。 私たちのボードにはFlexSPIコントローラにコネクテッドされた2つのMT35XU512ABAフラッシュチップがあります。基板の回路図から、XSPI_A_DQS信号がフラッシュ(ピンC3)からLX2160Aにルーティングされていることが確認できます プロセッサ(ピンE23)。 しかし、DTRモードを使用しようとすると、フラッシュメモリの読み取り結果が不正なデータ(すべてゼロ)を返します。SDRのオクタルモード(1-8-8)は、様々な周波数で正しく動作します。 また、LinuxカーネルではLX2160A FlexSPIドライバが設定されていることにも気づきましたFSPI_QUIRK_DISABLE_DTR。 https://lists.infradead.org/pipermail/linux-mtd/2022-July/094127.html もう少し詳しく教えていただけますか: 1. LX2160A FlexSPIコントローラはDTR/DDRモード用のDQSベースのデータサンプリングをサポートしていますか?それともこれはシリコンの限界として知られていますか? 2. シリコンでDQSをサポートしていない場合、RDBボード上のXSPI_A_DQSピン配線の目的は何でしょうか? 3. DTRモードが機能する設定や訂正表はありますかLX2160A? 理事会:LX2160A-RDB Rev B フラッシュ:MT35XU512ABA(*2、オクタル) リファレンスマニュアル:LX2160Aリファレンスデザインボードリファレンスマニュアル、Rev. 5、2021年9月28日 クラウド・ラボ オンラインデバッグ オンラインラボ 仮想テスト Re: FlexSPI DDR/DTR mode support on LX2160A - DQS clarification needed MT35XU512ABAには、Xccelaと呼ばれる特定のSPIプロトコルが搭載されます。LX 2160Aがサポートできるかどうかは分かりません Re: FlexSPI DDR/DTR mode support on LX2160A - DQS clarification needed こんにちは、 実際の答えとしては、NXPがシリコンリビジョン特有の回避策を認めない限り、Linux/LSDKのLX2160A-RDB上のオクタルDTRはサポートされていないとみなすことです。最も強力な実装証拠は、あなたが見つけたNXP Linuxパッチです。そこでは「lx2160aはDQSを実装していない」という理由でLX2160A FSPI_QUIRK_DISABLE_DTR が追加され、これがOctal DTRモードでフラッシュプローブの失敗を引き起こすと書かれています。 ご質問にお答えします。 FlexSPI LX2160A DQSベースのDTR/DDRサンプリングをサポートしていますか? リファレンスマニュアルでは、FlexSPI IPがDQS/リードストロボサンプリングモードを持つと説明されており、 MCR0[RXCLKSRC] = 0x3 「フラッシュ提供のリードストロボとDQSパッドからの入力」を選択し、入力タイミングセクションにはフラッシュ提供のリードストロボによるサンプリングが明示的に説明されています。しかし、LinuxプラットフォームのLX2160Aデータは「DQSを実装していない」としてDTRを無効化しています。ですので、汎用的なFlexSPIのIP説明だけでシリコンが外部DQSをオクタルDTRに使える証拠LX2160Aないと思います。 LX2160A-RDBでは、なぜ XSPI_A_DQS ルーティングされているのですか? DQSピンは、フラッシュメモリから提供される読み出しストロボであるだけでなく、マニュアルでは A_DQS 複数の機能を持つI/Oとして説明されています:外部読み取りストローブ、レイテンシ情報、ループバックダミー読み取りストローブなどです。また、このピンの基板レベルの負荷をループバックモードでのデータ/SCLKロードを補正することも可能だと記されています。同じFlexSPIブロックは、一部の書き込み操作において、書き込みマスク関連の信号としてDQS/RWDSも使用する。したがって、RDBルーティングはFlexSPIのピン/機能セットおよびボード互換性と整合していますが、それだけでは外部DQSベースのオクタルDTR読み取りをサポートしているLX2160A証明できません。 LX2160AでDTRを有効にするための設定や修正プログラムはありますか? DQS モードのドキュメントに記載されている構成は、 MCR0[RXCLKSRC] = 0x3 で、フラッシュメモリから提供される読み出しストローブを使用する場合は、DLL 設定として SLVDLYTARGET=0xF 、 DLLEN=1 、 OVRDEN=0 なります。シリアル ルート クロックが 100 MHz 未満の場合、マニュアルには、DLL オーバーライド モードを OVRDEN=1 で使用し、 OVRDVAL 調整するように記載されています。N N = 18 は推奨値として示されていますが、調整が必要になる場合があります。しかし、LX2160A特有のLinuxのクセは、LX2160AでDQSが実装されていないためDTRが無効化されていると言っており、LX2160Aリファレンスマニュアル/データシート資料、RDBリファレンスマニュアル、NXP/Linuxパッチテキスト、公開エラッタスタイルの検索を確認した後でも、DQS/DTRを再有効化するLX2160Aエラタや文書化された回避策は見つかりませんでした https://lists.infradead.org/pipermail/linux-mtd/2022-July/094127.html ドライバの推奨位置:LX2160AはSDRオクタル 1-8-8 を使い、 FSPI_QUIRK_DISABLE_DTR を保持してください。 あなたの症状(SDR Octalは動作するが、DTRの読み取りでゼロが返される)は、単純な基板配線の問題ではなく、このSoCでDTRをブロックするという上流側の決定と一致しています。 よろしくお願いします。
View full article