Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
Huge power consumption on RTC ofLPCXpresso54S018M EVB. I use are LPCXpresso54S018M EVB. I need the RTC in the LPC54018 to work after the main power supply is removed. I initialized and enabled the RTC in my firmware. I powered the VBATT line (J10:11) with a coin cell battery CR2032. While the main power is present, the VBATT line consumption is == 0. It's Ok. However, after removing the main power supply, the VBATT line consumption increases up to ~41 uA! According to the datasheet, consumption should be less than 1 uA. Why? How can I achieve current consumption of 1 µA or less? LPC54xxx Re: Huge power consumption on RTC ofLPCXpresso54S018M EVB. Hi @jcxz  The ~41 µA is most likely leakage through the RESETN circuitry , not RTC consumption. When main power is removed, VBAT > VDD; If VBAT> VDD, the external reset pin must be floating to prevent high VBAT leakage. The LPCXpresso54S018M-EVK connects RESETN to its pushbutton/debug circuitry, so the unmodified EVK does not satisfy that measurement condition. To reduce the current: Isolate the MCU’s RESETN pin from the EVK reset network. BR Harry Re: Huge power consumption on RTC ofLPCXpresso54S018M EVB. I read about this requirement in the datasheet (If VBAT> VDD, the external reset pin must be floating to prevent high VBAT leakage). But I don't understand how to achieve this? I'm not talking about a EVB schematic. EVB - only for prototyping. But in our working device's circuit, MCU RESETN will be connected direct to the RST output of the external WDT-chip (TPS3823-33DBVR). Can you recommend: How to correct the connection MCU.RESETN <-> WDT.RST connection's schematic so, that the VBAT current consumption does not exceed 1 µA? I am attaching a schematic of the WDT <-> MCU.RESETN interconnection in my device: In this picture, the wire named "Reset" is connected to the RESETN pin of the LPC54005JBD100. Re: Huge power consumption on RTC ofLPCXpresso54S018M EVB. Hi @jcxz  "Floating" here means that RESETN should have no external DC path during battery-only operation (VBAT present, VDD removed). The MCU's internal reset pull-up does not need to be disabled; the datasheet already accounts for that condition. In the proposed watchdog circuit, RESETN remains connected to the unpowered TPS3823 output as well as the external RC network. Therefore, the datasheet condition of a floating RESETN pin is not met. This is a plausible explanation for the observed ~41 µA current, although the exact leakage path has not yet been experimentally verified. To meet the datasheet condition, we recommend inserting a normally-open isolation switch between the watchdog reset output and the MCU RESETN pin. All external reset components (pull-up resistor, capacitor, watchdog output, etc.) should remain on the watchdog side of the switch, while the MCU side should not contain any external pull-up, pull-down, capacitor, or other DC connection. The selected switch should explicitly support a low-leakage, high-impedance state when its supply voltage is removed. BR Harry
查看全文
LPCXpresso54S018M EVB 的 RTC 功耗巨大。 我使用的是 LPCXpresso54S018M EVB。我需要 LPC54018 中的 RTC 在主电源断开后仍然能够工作。我在固件中初始化并启用了实时时钟 (RTC)。我用一枚纽扣电池 CR2032 为 VBATT 线 (J10:11) 供电。主电源正常时,VBATT 线路功耗为 0。没问题。然而,移除主电源后,VBATT 线功耗增加到约 41 uA!根据数据手册,功耗应小于 1 uA。为什么?如何才能实现1µA或更低的电流消耗? LPC54xxx Re: Huge power consumption on RTC ofLPCXpresso54S018M EVB. 我在数据手册中读到了这个要求(如果 VBAT> VDD,则外部复位引脚必须悬空,以防止 VBAT 漏电流过高)。 但我不知道该如何实现这一点? 我说的不是EVB原理图。EVB——仅用于原型制作。但在我们的工作设备电路中,MCU RESETN 将直接连接到外部 WDT 芯片 (TPS3823-33DBVR) 的 RST 输出。 请问如何修正MCU.RESETN <-> WDT.RST连接的原理图,才能使VBAT电流消耗不超过1 µA? 我附上设备中 WDT <-> MCU.RESETN 互连的原理图: 在这张图中,名为“Reset”的导线连接到 LPC54005JBD100 的 RESETN 引脚。 Re: Huge power consumption on RTC ofLPCXpresso54S018M EVB. 嗨@jcxz ~41 µA 很可能是 RESETN 电路的漏电流,而不是 RTC 的功耗。主电源断开时,VBAT > VDD;如果 VBAT > VDD,则外部复位引脚必须浮空,以防止 VBAT 漏电流过高。 LPCXpresso54S018M-EVK 将 RESETN 连接到其按钮/调试电路,因此未修改的 EVK 不满足该测量条件。 为了降低电流: 将 MCU 的 RESETN 引脚与 EVK 复位网络隔离。 BR 哈里 Re: Huge power consumption on RTC ofLPCXpresso54S018M EVB. 嗨@jcxz “浮空”在此表示 RESETN 在仅使用电池供电时(VBAT 存在,VDD 移除)不应有外部直流通路。MCU 的内部 RESET 上拉电阻无需禁用;数据手册已经考虑到了这种情况。 在所提出的看门狗电路中,RESETN 仍然连接到未通电的 TPS3823 输出以及外部 RC 网络。因此,数据手册中关于 RESETN 引脚浮空的条件不满足。对于观察到的 ~41 µA 电流,这是一种合理的解释,尽管确切的泄漏路径尚未通过实验验证。 为了满足数据手册的要求,我们建议在看门狗复位输出和 MCU RESETN 引脚之间插入一个常开隔离开关。所有外部复位元器件(上拉电阻、电容、看门狗输出等)都应保留在开关的看门狗侧,而 MCU 侧不应包含任何外部上拉、下拉、电容或其他直流连接。 所选开关应明确支持在电源电压移除时处于低漏电、高阻抗状态。 BR 哈里
查看全文
Recommendation for NXP i.MX Processor for 1080p RTSP IP Camera Hi everyone, Could anyone suggest the lowest cost NXP i.MX processor that can handle a 1080p RTSP IP camera stream? My requirements are:     1 RTSP IP camera input    2 1080p resolution    3 Around 25–30 FPS    4 Looking for the lowest-cost i.MX processor/board that can handle this reliably The main goal is to receive and process/display a  1080p RTSP camera stream at the lowest possible hardware cost. If anyone has tested a low-cost i.MX processor for a similar use case, please share your recommendation and experience. Thanks! Re: Recommendation for NXP i.MX Processor for 1080p RTSP IP Camera Hello, For a pure receive/display application using an IP Camera, you can consider i.MX8MM since includes a dedicated hardware VPU capable of 1080p60 decode. Best regards.
查看全文
在 macOS 上,RT685 DSP 镜像使用缓存的二进制文件,而不是在 Zephyr sysbuild 中新构建的二进制文件。 平台:MacOS 15.6.1 (24G90) VS Code(版本:1.112.0)(普遍的)) MCUXpresso for VS Code: 26.8.29 Zephyr 工具链:zephyr-sdk-1.0.1,zsdk nxp-v4.4.1.1 应用程序:amp_blinky 已作为zephyr-freestanding导入 开发板:MIMXRT685-EVK 说明: 我正在MacOS上搭建开发环境,同样的步骤在我的Linux机器上运行良好。虽然使用 MCUXpresso进行构建和烧录时没有出现任何严重警告/错误,但应用程序在 Arm 和 DSP 内核上都能正常运行。然后我编辑了 remote/src 和 remote/prj.conf 下的代码,并在全新版本后将其刷入。然而,DSP 核心在编辑之前仍然运行了之前的图像。 以下是一些有趣的行为: 我也尝试修改了 Arm 核心代码,但更改已成功应用。 DSP核心代码的更改可能会触发非初始版本,而不是显示“无需工作”。 禁用 cmake 中的 CCACHE 似乎可以解决问题。 就目前来看,这似乎是一个与缓存相关的问题,编译器在运行 sysbuild 时忽略了 DSP 映像中的更改,并使用了缓存的二进制文件,无论它是否已被重新构建。这可能是由于 nxp_zephyr/zephyr/samples/boards/nxp/adsp/rtxxx/common/src/dspimgs.S 没有更新造成的。另外,这可能只是 macOS 系统的问题,因为我在 Linux 机器上没有发现这个问题。 这是已知问题吗?除了禁用 CCACHE 之外,有没有更优雅的解决方案? 顺祝商祺! 岳 ZEPHYR-OS-EDGE i.MX RT600 Re: RT685 DSP image uses cached binary instead of newly built in Zephyr sysbuild on MacOS 尊敬的@YueZ , 谢谢你的提问。 目前为止,我们这边还没有发现这个问题。 为了帮助找出根本原因,请您检查以下输出是否持续更新? 远程版本过程生成的 DSP BIN。 由 dspimgs.S 生成的对象文件 最终实际编程到设备上的 Arm BIN。 如果 DSP BIN 已更新,但从 dspimgs.S 生成的目标文件尚未更新,则一个可能的原因是构建系统没有更新 DSP BIN 时间戳。因此,依赖项检查可能跳过了重新编译 dspimgs.S。 我们建议将以下内容添加到负责 dspimgs.S 的CMake配置中,以确保 DSP BIN 中的更改触发重新构建: 设置(DSP_BIN_DIR ${CMAKE_BINARY_DIR} /../remote/zephyr) 设置属性(源) ${CMAKE_CURRENT_SOURCE_DIR} /src/dspimgs.S 属性 OBJECT_DEPENDS ${DSP_BIN_DIR} /zephyr_reset.bin ${DSP_BIN_DIR} /zephyr_text.bin ${DSP_BIN_DIR} /zephyr_data.bin ) (请同时确认文件路径是否正确。) 如有任何疑问,请与我们联系。   顺祝商祺! 雪莉 Re: RT685 DSP image uses cached binary instead of newly built in Zephyr sysbuild on MacOS 你好,雪莉, 谢谢你的回复! 我检查了 build/remote/zephy 下的三个 DSP BIN、最终的 Arm BIN 以及 build/amp_blinky/CMakeFiles/app.dir/.../adsp/rtxxx/common/src/ 下的 dspimgs.S.obj 的时间戳,它们都被原始构建或非原始构建更新了。 我还尝试了推荐的 CMake 配置,方法是替换 设置源文件属性( " ${CMAKE_CURRENT_LIST_DIR} /src/dspimgs.S" 对象依赖项 ${HIFI4_BUILD_DIR} /zephyr.elf )   (带   设置(HIFI4_BIN_DEPS) " ${HIFI4_BUILD_DIR} /zephyr.elf" " ${HIFI4_BUILD_DIR} /zephyr.reset.bin" " ${HIFI4_BUILD_DIR} /zephyr.text.bin" " ${HIFI4_BUILD_DIR} /zephyr.data.bin" ) 设置源文件属性( " ${CMAKE_CURRENT_LIST_DIR} /src/dspimgs.S" Properties 对象依赖项 " ${HIFI4_BIN_DEPS} " ) 在 dsp-load.cmake 中,并通过以下方式验证了更改: `ninja -C build/amp_blinky -t query build/.../dspimgs.S.obj`   但遗憾的是,这个问题依然存在。然后我又做了如下测试: 在 remote/src/main.c 中添加 ` printk ( " TESTCCACHE " );` 构建 调用 `strings build/.../dspimgs.S.obj | grep TESTCCACHE` 调用 `strings build/remote/zephyr/zephyr.text.bin build/remote/zephyr/zephyr.data.bin | grep TESTCCACHE` 步骤 3 没有返回任何结果,而步骤 4 找到了字符串。然后,我禁用 CCACHE 后再次运行测试,结果在两次测试中都发现了 TESTCCACHE。看起来,当启用 CCACHE 时,dspimgs.S.obj 的时间戳已更新,但没有加载正确的二进制文件。 欢迎大家就此发表意见。 顺祝商祺! 岳 Re: RT685 DSP image uses cached binary instead of newly built in Zephyr sysbuild on MacOS 尊敬的@YueZ , 请尝试: CCACHE_RECACHE=1?   与 CCACHE_DISABLE 完全绕过 ccache 并执行完全重建而不读取或写入任何缓存条目不同,CCACHE_RECACHE=1 强制重新生成所有输出,并使用新构建的结果更新缓存。 如果使用 CCACHE_RECACHE=1 后问题消失,则表明根本原因可能是缓存内容过旧。如果问题仍然存在,则表明问题与 ccache 本身有关,而不是与特定的缓存条目有关。 顺祝商祺! 雪莉   Re: RT685 DSP image uses cached binary instead of newly built in Zephyr sysbuild on MacOS 你好,雪莉, 是的, CCACHE_RECACHE=1 可以正常工作。 顺便说一下,我通过在 CMakeLists 中将 USE_CCACHE 设置为 0 来禁用 CCACHE。至于 CCACHE_DISABLE,我必须在 West 工作区的终端中显式设置才能使其生效,这对于在 VS Code 中使用 MCUXpresso 来说不太理想。CCACHE_RECACHE 也存在同样的问题,我无法通过将其添加到 CMakeLists 中来使用它。 顺祝商祺! 岳
查看全文
Correct snvs_cfg values for TAMPER_OUT0/TAMPER_IN4 active tamper loop on i.MX8DXL EVK (J20) Hi, I'm validating the external active-tamper loop on the i.MX8DXL EVK (MCIMX8DXL-WEVK) via U-Boot. From the board schematic, I've confirmed J20 (TAMPER header, 1x3) is wired as: - Pin 1 = TAMPER_IN4 (net SNVS.TAMPER_IN4, ball AJ13) - Pin 2 = GND - Pin 3 = TAMPER_OUT0 (net SNVS.TAMPER_OUT0, ball AP22) These are dedicated SNVS pins, not shared with SAI2/SAI3 like TAMPER_OUT1-4/IN0-3. Available U-Boot commands: tamper_pin_cfg, snvs_cfg (with sub-registers hp.lock, hp.secvio_intcfg, hp.secvio_ctl, lp.lock, lp.secvio_ctl, lp.tamper_filt_cfg, lp.tamper_det_cfg, lp.tamper_det_cfg2, lp.tamper_filt1_cfg, lp.tamper_filt2_cfg, lp.act_tamper1_cfg through lp.act_tamper5_cfg, lp.act_tamper_ctl, lp.act_tamper_clk_ctl, lp.act_tamper_routing_ctl1, lp.act_tamper_routing_ctl2), snvs_sec_status, snvs_clear_status. Since TAMPER_OUT0/TAMPER_IN4 form an active tamper pair, my questions: 1. Which lp.act_tamperN_cfg channel (1-5) corresponds to TAMPER_OUT0? 2. What values for lp.act_tamper_routing_ctl1/routing_ctl2 route TAMPER_OUT0's pattern to be checked against TAMPER_IN4? 3. What value for lp.act_tamper_clk_ctl enables the pattern clock for this channel? 4. What value for lp.act_tamper_ctl globally enables active tamper detection for this channel? Goal: closing a jumper across J20 pins 1-3 should read as secure in snvs_sec_status, and opening it should trigger a violation. Is there a reference test procedure or app note for external active tamper validation on i.MX8DXL? Thanks!
查看全文
LIBUSB_ERROR_NO_DEVICE こんにちは、 フラッシュ中に問題が発生しています。IMX8MPプロセッサを使っています。 vougavent@vougavent-work-station1:~/Desktop/imx-yocto-bsp/build-wayland2/tmp/deploy/images/imx8mp-lpddr4-evk$ sudo uuu -v -b emmc_all imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evkcore-image-weston-imx8mp-lpddr4-evk-20260725065928.rootfs.wic.bz2 NXP IMXチップ用uuu(Universal Update Utility)--lib1.4.193 設定ファイルに含める: PctlチップビデオPID Bcdバージョン ================================================== SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff] SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff] SDPS: MX8DXL 0x1fc9 0x0147 SDPS: MX28 0x15a2 0x004f SDPS: MX815 0x1fc9 0x013e SDPS: MX865 0x1fc9 0x0146 SDPS: MX8ULP 0x1fc9 0x014a SDPS: MX8ULP 0x1fc9 0x014b SDP: MX7D 0x15a2 0x0076 SDP: MX6Q 0x15a2 0x0054 SDP: MX6D 0x15a2 0x0061 SDP: MX6SL 0x15a2 0x0063 SDP: MX6SX 0x15a2 0x0071 SDP: MX6UL 0x15a2 0x007d SDP: MX6ULL 0x15a2 0x0080 SDP: MX6SLL 0x1fc9 0x0128 SDP: MX7ULP 0x1fc9 0x0126 SDP: MXRT106X 0x1fc9 0x0135 SDP: MX8MM 0x1fc9 0x0134 SDP: MX8MQ 0x1fc9 0x012b SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff] SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998] SDPV: SPL1 0x1fc9 0x0151 [0x0500..0x9998] SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999] SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff] SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998] FBK: 0x066f 0x9afe FBK: 0x066f 0x9bff FBK: 0x1fc9 0x0153 FB: 0x0525 0xa4a5 FB: 0x18d1 0x0d02 FB: 0x3016 0x0001 FB: 0x1fc9 0x0152 組み込みスクリプトを実行します: uuu_version 1.4.149 # @_flash.bin |WICイメージから抽出できるブートローダー # @_image [_flash.bin]| wicイメージをemmcに書き込む。 # このコマンドは i.MX6/7 i.MX8MM, i.MX8MQ の時に実行されます。 SDP: boot -f imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk-scanlimited 0x800000 # このコマンドはROMがストリームモードをサポートするときに実行されます # i.MX8QXP、i.MX8QM SDPS: boot -scanterm -f imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk-scanlimited 0x800000 # これらのコマンドはSPLを使用する場合に実行され、SPLを使用しない場合はスキップされます # SDPU は非推奨になります。SDPUではなくSDPVを使用してください # { SDPU:遅延1000 SDPU: write -f imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk-オフセット 0x57c00 SDPU: ジャンプ -scanlimited 0x800000 # } # これらのコマンドはSPLを使うときに実行され、SPLがなければスキップされます # もし(SPLがSDPVをサポートする場合) # { SDPV:ディレイ1000 SDPV: write -f imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk-skipspl -scanterm -scanlimited 0x800000 SDPV: ジャンプ -scanlimited 0x800000 # } FB: ucmd setenv fastboot_dev mmc FB: ucmd setenv mmcdev ${emmc_dev} FB: ucmd MMC開発 ${emmc_dev} FB: flash -raw2sparse all core-image-weston-imx8mp-lpddr4-evk-20260725065928.rootfs.wic.bz2/* FB: flash -scanterm -scanlimited 0x800000 ブートローダー imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi; FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0 FB: 完了 既知のUSBデバイスが表示されるまで待つ... 新しいUSBデバイスを1:10に接続 1:10>Start Cmd:SDPS: boot -scanterm -f imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk-scanlimited 0x800000 33%1:10>HID(W)エラー:LIBUSB_ERROR_NO_DEVICE(0.786秒) i.MX 8ファミリ | i.MX 8QuadMax (8QM) | 8QuadPlus Re: LIBUSB_ERROR_NO_DEVICE こんにちは、 NXP Semiconductors製品にご関心いただきありがとうございます。 あなたのシステム構成では、カスタムボードを使用していますか、それともi.MX 8M Plus EVKを使用していますか?カスタムボードを使用している場合は、メモリと電力の必要な差異に焦点を当てて、必要なコードを修正することをお勧めします。次に、番号ポータビリティが有効であり、適用されていることを確認します。 このエラーは、無効なimx-bootファームウェアイメージを使う場合に現れます。他にもケーブルの不良やUSB電源のリセットなどが原因かもしれません。壁掛け式USB充電器を使うのも手です。 よろしくお願いいたします。 Re: LIBUSB_ERROR_NO_DEVICE こんにちは、 @JosephAtNXP さん。 ご迷惑をおかけして申し訳ありません。単純な電流不足が原因でした。電流を必要なレベルまで上げたところ、すべて正常に動作するようになりました。
查看全文
将自定义模型从 S32K3xx MBDT 1.5.0 迁移到 1.8.0,硬件设置错误 您好,NXP支持团队, 我们需要您的帮助,将现有的 Simulink 模型从 S32K3xx 的基于模型的设计工具箱 1.5.0 版迁移到 1.8.0 版。 我们的模型集成了我们自定义的 IOC 工具箱,之前一直使用 MBDT 1.5.0 版本。升级到 1.8.0 版本后,在使用 MATLAB/Simulink R2024b 时,我们的工程师在打开模型的硬件设置时遇到了错误。 重现步骤如下: 1. 安装适用于 S32K3xx 的 MBDT 版本 1.8.0。 2. 打开我们现有的演示模型,IOC_DemoPrj.slx。 3. 选择硬件 → 硬件设置。 “配置参数”对话框无法打开,并显示以下错误: 输出参数“out”(以及其他可能的参数)未赋值 在执行“mbd_s32k3.nxp.target.get_target_memory_entries”时 功能。 对话框中还提到了 getTargetHardwareDetailWidgets.p。请查看附件截图以获取完整信息。 我们已就此问题联系了 MathWorks 技术支持,案例编号为 #09014041。他们建议我们咨询 NXP,因为 MBDT 插件是由 NXP 开发的;根本原因尚未得到确认。 请问您能否帮我们解决以下问题? 1. 迁移流程:将模型从 MBDT 1.5.0 迁移到 1.8.0 的支持流程是什么?是否有迁移指南或转换工具可用,我们是否可以直接升级? 2. 错误诊断:get_target_memory_entries 错误是已知问题吗?是否有适用的补丁或解决方法? 3. 现有配置:该型号的硬件、目标内存或外设配置是否需要转换或重新生成?如果需要,在无法打开硬件设置的情况下,我们应该如何执行此操作? 4. 自定义 IOC 工具箱:这些版本之间的哪些更改可能需要更新我们的自定义模块、模型回调或构建集成?请指出相关的接口和建议的更改。 5. 诊断信息:您需要哪些模型文件、配置文件、日志和安装详细信息来确定这是迁移问题、安装/路径问题还是自定义工具箱集成问题? 我们的目标是保留现有的 IOC 功能,并进行必要的更改,以便使用 MBDT 1.8.0 成功配置、构建和运行模型。 谢谢。
查看全文
MCXN947 DLLの自動調整機能が動作しません こんにちは、 私はFlexSPI経由でMCXN947とOctalRAM(IS66WVO32M8DALL-200BLI)を使用しています。 FlexSPIのルートクロックはPLL1を介して150MHzで供給され、RAMはDDRモードで動作するため、出力クロックレートは75MHzになります。 `flexspi_device_config_t`には以下のパラメータがあります。 flexspi_device_config_t psram_config = { .flexspiRootClk = 150000000U, .isSck2Enabled = false, .flashSize = OCTALRAM_ISSI_SIZE, .CSIntervalUnit = kFLEXSPI_CsIntervalUnit1SckCycle, .CSInterval = 2, .CSHoldTime = 2, .CSSetupTime = 2, .dataValidTime = 2, .columnspace = 4, .enableWordAddress = false, .AWRSeqIndex = HYPERRAM_CMD_LUT_SEQ_IDX_WRITEDATA, .AWRSeqNumber = 1, .ARDSeqIndex = HYPERRAM_CMD_LUT_SEQ_IDX_READDATA, .ARDSeqNumber = 1, .AHBWriteWaitUnit = kFLEXSPI_AhbWriteWaitUnit2AhbCycle, .AHBWriteWaitInterval = 0, .enableWriteMask = true, }; FlexSpiの初期化には、SDK FLEXSPI_DRIVERバージョン2.6.0を使用しています。 自動調整機能(マニュアル10.3.15.6節「サンプリングのためのDLL構成」)でディレイセルを以下の値で設定すると、 • SLVDLYTARGET=0x0F(分算器16/32 * root_clock = 3.33 ns) • REFPHASEGAP=0x02 • DLLEN=0x01 • OVRDEN=0x01 ASLVLOCKとAREFLOCKのロックビットを待った後、ASLVSELには0x01、AREFSELには0x00が返されました。その結果、設定された遅延時間が約120psであるため、RAMの読み書き機能は動作しません。 /* Configure DLL. */ configValue = FLEXSPI_CalculateDll(base, config); base->DLLCR[index] = configValue; /* DLL neu kalibrieren */ base->DLLCR[0] |= FLEXSPI_DLLCR_DLLRESET_MASK; base->DLLCR[0] &= ~FLEXSPI_DLLCR_DLLRESET_MASK; /* Exit stop mode. */ base->MCR0 &= ~FLEXSPI_MCR0_MDIS_MASK; /* Lock abwarten */ while ((base->STS2 & (FLEXSPI_STS2_AREFLOCK_MASK | FLEXSPI_STS2_ASLVLOCK_MASK)) != (FLEXSPI_STS2_AREFLOCK_MASK | FLEXSPI_STS2_ASLVLOCK_MASK)) { } SDK_DelayAtLeastUs(10U, CLOCK_GetCoreSysClkFreq()); SLVDLYTARGETに異なる値を使用しても、ASLVLOCKとAREFLOCKの出力は変わりません。 しかし、レジスタOVRDEN=0x01とOVRDVAL=0x1bを使用して遅延時間を固定値(約3.36ナノ秒の遅延時間に相当)に設定すると、RAMからの読み書きは問題なく動作します。 しかし、ルートクロックが100 MHzを超えるため、NXPはDLLの自動調整機能の使用を推奨しています。 残念ながら、正しい遅延時間を判断できないようです! 通信・制御(I3C |I2C |SPI |FlexCAN |イーサネット |FlexIO) コアとメモリ MCX N Re: MCXN947 DLL auto-adjusted function not working こんにちは、 @IbhDanielさん 投稿ありがとうございます! MCXNx4リファレンスマニュアルによると、シリアルルートクロックはFlexSPIコアクロックであることが示されています(表79参照)。時計の使用状況)。あなたの場合、このクロックは150 MHzに設定されています。 また、DLLサンプリング構成を実装しており、自動キャリブレーションパスが正しいアプローチのようです。設定値SLVDLYTARGET = 0x0FおよびDLLEN = 0x01は正しく構成されています。唯一特定された問題は、OVRDENが0x00ではなく0x01であり、これにより自動キャリブレーション出力経路が無効化され、SLVDLYTARGET値に関係なくASLVSEL=0x01、AREFSEL=0x00となります。 上記の分析結果が貴社の実装にも当てはまるかどうか確認させてください。以下を確認してください:MCR0[RXCLKSRC] = 3h(フラッシュメモリ提供の読み取りストロボとDQSパッドからの入力)があなたの構成で使用されているか? Re: MCXN947 DLL auto-adjusted function not working こんにちは、カルロスさん。 ご返信ありがとうございます。 すみません、誤字で、OVRDENビットを0に設定しました。MCUレジスタのスクリーンショットを見ると、OVRDENが値0に設定されているのもわかります。 私はOctalRam IS66WVO32M8DALL-200BLIを使っています。もし理解が正しければ、このモジュールはDQS信号をMCUに送っているようです。 Re: MCXN947 DLL auto-adjusted function not working 再度確認したところ、MCUのMCR0[RXCLKSRC]ビットは3時間に設定されています。 Re: MCXN947 DLL auto-adjusted function not working こんにちは、 @IbhDaniel さん。 あなたの構成でMCR0[RXCLKSRC] = 3h(DQSパッドからのフラッシュメモリ提供の読み取りストロボ入力)が使われているか確認していただけますか? この点は重要です。なぜなら、自動調整・キャリブレーションはDQS信号が外部DQSパッドから送信される場合にのみサポートされるからです。RXCLKSRCの設定が異なると、自動遅延調整機構は期待どおりに動作しません。
查看全文
SW32K14-MCAL421-RTMC-1.0.1 の FlexNet 利用権を申請してください。 こんにちは、NXPサポートチームの皆さん、 以下のアクセスを申請したいのです: SW32K14-MCAL421-RTMC-1.0.1 ターゲットMCU:S32K144 AUTOSAR MCAL: 4.2.x 既存の提案に提案された解決策はすでに採用しています NXPコミュニティのトピック: 1.nxp.com で「S32K1 MCAL」を検索してFlexeraと入力しました 公式製品ページを通じて。 2. また、直接リンクも試してみました。 SW32K14-MCAL421-RTMC-1.0.1 をNXPアカウントにログインした状態で実行します。 しかし、「前へ」タブはまだグレー表示されており、直接 リンク先の表示: 商品が見つからなかったか、またはあなたに権限がありません。 このアイテムをダウンロードするには。」 また、NXPサポートCASEの作成も試みましたが、CASE ポータルには「CASE作成が無効」と表示されています。メールアドレスが原因で NXPについてと連携してはいけません。 どうやら私のNXPアカウントは現在アクセスできないようです このパッケージの権利/FlexNet権利について。 ぜひ追加でお願いできますか? SW32K14-MCAL421-RTMC-1.0.1 私のNXPアカウントに、またはアクセス方法を教えてください レガシーリリース? サポートありがとうございます。 よろしくお願いいたします。 Re: Request FlexNet entitlement for SW32K14-MCAL421-RTMC-1.0.1 こんにちは@pikaqiu 今すぐお試しください: https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K1-MCAL-D しかし、このソフトウェアは現在サポートおよびメンテナンスされていません。最新のRTDドライバの使用を推奨します。 よろしくお願いいたします。 ルーカス
查看全文
LIBUSB_ERROR_NO_DEVICE Hi, I am having an issue while flashing.i am using an imx8mp processor. vougavent@vougavent-work-station1:~/Desktop/imx-yocto-bsp/build-wayland2/tmp/deploy/images/imx8mp-lpddr4-evk$ sudo uuu -v -b emmc_all imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk core-image-weston-imx8mp-lpddr4-evk-20260725065928.rootfs.wic.bz2 uuu (Universal Update Utility) for nxp imx chips -- lib1.4.193 Build in config: Pctl Chip Vid Pid BcdVersion ================================================== SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff] SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff] SDPS: MX8DXL 0x1fc9 0x0147 SDPS: MX28 0x15a2 0x004f SDPS: MX815 0x1fc9 0x013e SDPS: MX865 0x1fc9 0x0146 SDPS: MX8ULP 0x1fc9 0x014a SDPS: MX8ULP 0x1fc9 0x014b SDP: MX7D 0x15a2 0x0076 SDP: MX6Q 0x15a2 0x0054 SDP: MX6D 0x15a2 0x0061 SDP: MX6SL 0x15a2 0x0063 SDP: MX6SX 0x15a2 0x0071 SDP: MX6UL 0x15a2 0x007d SDP: MX6ULL 0x15a2 0x0080 SDP: MX6SLL 0x1fc9 0x0128 SDP: MX7ULP 0x1fc9 0x0126 SDP: MXRT106X 0x1fc9 0x0135 SDP: MX8MM 0x1fc9 0x0134 SDP: MX8MQ 0x1fc9 0x012b SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff] SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998] SDPV: SPL1 0x1fc9 0x0151 [0x0500..0x9998] SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999] SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff] SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998] FBK: 0x066f 0x9afe FBK: 0x066f 0x9bff FBK: 0x1fc9 0x0153 FB: 0x0525 0xa4a5 FB: 0x18d1 0x0d02 FB: 0x3016 0x0001 FB: 0x1fc9 0x0152 Run built-in script: uuu_version 1.4.149 # @_flash.bin | bootloader, which can extract from wic image # @_image [_flash.bin] | wic image burn to emmc. # This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ SDP: boot -f imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk -scanlimited 0x800000 # This command will be run when ROM support stream mode # i.MX8QXP, i.MX8QM SDPS: boot -scanterm -f imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk -scanlimited 0x800000 # These commands will be run when use SPL and will be skipped if no spl # SDPU will be deprecated. please use SDPV instead of SDPU # { SDPU: delay 1000 SDPU: write -f imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk -offset 0x57c00 SDPU: jump -scanlimited 0x800000 # } # These commands will be run when use SPL and will be skipped if no spl # if (SPL support SDPV) # { SDPV: delay 1000 SDPV: write -f imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk -skipspl -scanterm -scanlimited 0x800000 SDPV: jump -scanlimited 0x800000 # } FB: ucmd setenv fastboot_dev mmc FB: ucmd setenv mmcdev ${emmc_dev} FB: ucmd mmc dev ${emmc_dev} FB: flash -raw2sparse all core-image-weston-imx8mp-lpddr4-evk-20260725065928.rootfs.wic.bz2/* FB: flash -scanterm -scanlimited 0x800000 bootloader imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi; FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0 FB: done Wait for Known USB Device Appear... New USB Device Attached at 1:10 1:10>Start Cmd:SDPS: boot -scanterm -f imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk -scanlimited 0x800000 33%1:10>Fail HID(W):LIBUSB_ERROR_NO_DEVICE(0.786s) i.MX 8 Family | i.MX 8QuadMax (8QM) | 8QuadPlus Re: LIBUSB_ERROR_NO_DEVICE Hi, Thank you for your interest in NXP Semiconductor products, In your setup do you use a custom board or an i.MX 8M Plus EVK? If you are using a custom board I would advise to modify the necessary code, focusing in memory and power necessary differences. Then confirming your porting is valid and being applied. The error is seen when using an invalid imx-boot firmware image, another reasons can be defective cables or some USB power sources reset, you could try using a wall mount USB charger. Regards, Re: LIBUSB_ERROR_NO_DEVICE Hi @JosephAtNXP , Sorry for the inconvenience,it was a simple current shortage that caused the issue,when i raised the current to the required level,everything is working fine.
查看全文
申请 SW32K14-MCAL421-RTMC-1.0.1 的 FlexNet 授权 您好,NXP支持团队, 我希望申请访问以下内容: SW32K14-MCAL421-RTMC-1.0.1 目标MCU:S32K144 AUTOSAR MCAL:4.2.x 我已经按照现有方案中建议的解决方案进行了操作。 NXP社区主题: 1.我在 nxp.com 上搜索了“S32K1 MCAL”,然后输入了 Flexera。 通过官方产品页面。 2. 我还尝试了直接链接 登录我的 NXP 帐户后,SW32K14-MCAL421-RTMC-1.0.1。 然而,“上一页”选项卡仍然呈灰色,无法点击。 链接显示: “要么未找到该物品,要么您未获得授权。” 下载此项目。 我还尝试创建了一个 NXP 支持案例,但是案例提交失败。 门户网站显示“案例创建已禁用”,因为我的电子邮件地址 无法与任何公司关联。 我的NXP账户目前似乎没有访问权限。 此软件包的权利/FlexNet授权。 请问您能否帮忙添加 SW32K14-MCAL421-RTMC-1.0.1 请告知我如何才能访问我的NXP账户,或者告诉我如何才能获得访问权限。 旧版本发布? 非常感谢您的支持。 顺祝商祺! Re: Request FlexNet entitlement for SW32K14-MCAL421-RTMC-1.0.1 嗨@pikaqiu 立即尝试: https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K1-MCAL-D 但是,该软件已停止支持和维护。我们建议使用最新的RTD驱动程序。 此致, Lukas
查看全文
Request FlexNet entitlement for SW32K14-MCAL421-RTMC-1.0.1 Hello NXP Support Team, I would like to request access to: SW32K14-MCAL421-RTMC-1.0.1 Target MCU: S32K144 AUTOSAR MCAL: 4.2.x I have already followed the solution suggested in the existing NXP Community topic: 1. I searched for "S32K1 MCAL" on nxp.com and entered Flexera through the official product page. 2. I also tried the direct link for SW32K14-MCAL421-RTMC-1.0.1 while logged into my NXP account. However, the "Previous" tab is still greyed out, and the direct link shows: "Either the item was not found, or you are not authorized to download this item." I also attempted to create an NXP Support Case, but the Case Portal shows "Case creation disabled" because my email address cannot be linked to a company. It appears that my NXP account does not currently have access rights / FlexNet entitlement for this package. Could you please help add SW32K14-MCAL421-RTMC-1.0.1 to my NXP account, or advise how I can obtain access to this legacy release? Thank you very much for your support. Best regards Re: Request FlexNet entitlement for SW32K14-MCAL421-RTMC-1.0.1 Hi @pikaqiu  Try it now: https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K1-MCAL-D However, this SW is not supported and maintained anymore. We recommend to use latest RTD drivers.  Regards, Lukas
查看全文
LIBUSB_ERROR_NO_DEVICE 您好, 我在刷机时遇到问题。我使用的是imx8mp处理器。 vougavent@vougavent-work-station1:~/Desktop/imx-yocto-bsp/build-wayland2/tmp/deploy/images/imx8mp-lpddr4-evk$ sudo uuu -v -b emmc_all imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evkcore-image-weston-imx8mp-lpddr4-evk-20260725065928.rootfs.wic.bz2 适用于 NXP imx 芯片的 uuu(通用更新实用程序)-- lib1.4.193 内置配置: PCTL芯片视频PID BCD版本 ================================================== SDPS:MX8QXP 0x1fc9 0x012f [0x0002..0xffff] SDPS:MX8QM 0x1fc9 0x0129 [0x0002..0xffff] SDPS:MX8DXL 0x1fc9 0x0147 SDPS:MX28 0x15a2 0x004f SDPS:MX815 0x1fc9 0x013e SDPS:MX865 0x1fc9 0x0146 SDPS:MX8ULP 0x1fc9 0x014a SDPS:MX8ULP 0x1fc9 0x014b SDP:MX7D 0x15a2 0x0076 SDP:MX6Q 0x15a2 0x0054 SDP:MX6D 0x15a2 0x0061 SDP:MX6SL 0x15a2 0x0063 SDP:MX6SX 0x15a2 0x0071 SDP:MX6UL 0x15a2 0x007d SDP:MX6ULL 0x15a2 0x0080 SDP:MX6SLL 0x1fc9 0x0128 SDP:MX7ULP 0x1fc9 0x0126 SDP:MXRT106X 0x1fc9 0x0135 SDP:MX8MM 0x1fc9 0x0134 SDP:MX8MQ 0x1fc9 0x012b SDPU:SPL 0x0525 0xb4a4 [0x0000..0x04ff] SDPV:SPL1 0x0525 0xb4a4 [0x0500..0x9998] SDPV:SPL1 0x1fc9 0x0151 [0x0500..0x9998] SDPU:SPL 0x0525 0xb4a4 [0x9999..0x9999] SDPU:SPL 0x3016 0x1001 [0x0000..0x04ff] SDPV:SPL1 0x3016 0x1001 [0x0500..0x9998] FBK:0x066f 0x9afe FBK:0x066f 0x9bff FBK:0x1fc9 0x0153 FB:0x0525 0xa4a5 FB:0x18d1 0x0d02 FB:0x3016 0x0001 FB:0x1fc9 0x0152 运行内置脚本: uuu_version 1.4.149 # @_flash.bin | 引导加载程序,可以从 WIC 镜像中提取 # @_image [_flash.bin]| 将 WIC 映像刻录到 EMMC。 # 此命令将在 i.MX6/7、i.MX8MM、i.MX8MQ 运行时运行 SDP:boot -f imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk-scanlimited 0x800000 # 当 ROM 支持流模式时,将运行此命令 # i.MX8QXP,i.MX8QM SDPS:boot -scanterm -f imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk-scanlimited 0x800000 # 这些命令将在使用 SPL 时运行,如果未使用 SPL 则会跳过。 # SDPU 将被弃用。请使用 SDPV 代替 SDPU # { SDPU:延迟 1000 SDPU:写入 -f imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk-偏移量 0x57c00 SDPU:跳转 -scanlimited 0x800000 # } # 这些命令将在使用 SPL 时运行,如果未使用 SPL 则会跳过。 # 如果(SPL 支持 SDPV) # { SDPV:延迟 1000 SDPV:写入 -f imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk-skipspl -scanterm -scanlimited 0x800000 SDPV:跳转 -scanlimited 0x800000 # } FB:ucmd setenv fastboot_dev mmc FB:ucmd setenv mmcdev ${emmc_dev} FB:ucmd mmc dev ${emmc_dev} FB: flash -raw2sparse all core-image-weston-imx8mp-lpddr4-evk-20260725065928.rootfs.wic.bz2/* FB:flash -scanterm -scanlimited 0x800000 bootloader imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk FB: ucmd 如果环境变量 emmc_ack 存在;则;否则设置环境变量 emmc_ack 为 0;结束; FB:ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0 FB:完成 等待已知 USB 设备出现…… 1:10 时连接了新的 USB 设备 1:10>启动命令:SDPS:boot -scanterm -f imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk-scanlimited 0x800000 33%1:10>失败 HID(W):LIBUSB_ERROR_NO_DEVICE(0.786秒) i.MX 8 系列 | i.MX 8QuadMax (8QM) | 8QuadPlus Re: LIBUSB_ERROR_NO_DEVICE 您好, 感谢您对恩智浦半导体产品的关注, 你的配置中使用的是定制主板还是 i.MX 8M Plus EVK?如果您使用的是定制电路板,我建议您修改必要的代码,重点关注内存和功耗方面的差异。然后确认您的转网是否有效并正在应用。 当使用无效的 imx-启动 固件映像时会出现此错误,其他原因可能是电缆故障或某些 USB 电源 RESET,您可以尝试使用壁式 USB 充电器。 此致, Re: LIBUSB_ERROR_NO_DEVICE 你好@JosephAtNXP , 给您带来不便,非常抱歉。问题只是简单的电流不足造成的,当我把电流提升到所需水平后,一切就正常了。
查看全文
カスタムモデルをS32K3xx MBDT 1.5.0から1.8.0へ移行中ハードウェア設定エラー NXPサポートチームの皆さん、こんにちは。 既存のSimulinkモデルをModel-Based Design Toolbox for S32K3xxバージョン1.5.0からバージョン1.8.0へ移行する際のご協力をお願いしています。 当社のモデルはカスタムIOCツールボックスを組み込み、以前はMBDT 1.5.0で動作していました。MATLAB/Simulink R2024bを使用して1.8.0にアップグレードした後、エンジニアはモデルのハードウェア設定を開く際にエラーに直面しました。 再現手順は以下のとおりです。 1. S32K3xxバージョン1.8.0用のMBDTをインストールする。 2. 既存のデモモデル、IOC_DemoPrj.slxを開きます。 3. ハードウェア→ハードウェア設定を選択します。 設定パラメータダイアログが開かず、次のエラーが表示されます。 出力引数「out」(およびその他の引数)に値が割り当てられていません 「mbd_s32k3.nxp.target.get_target_memory_entries」を使用した実行において 関数。 このダイアログには、getTargetHardwareDetailWidgets.p への参照も含まれています。メッセージ全文については、添付のスクリーンショットをご覧ください。 私たちはCASE #09014041でMathWorksのテクニカルサポートに連絡しました。彼らはMBDTアドオンがNXPが開発しているため、NXPに相談するよう勧めました。根本原因はまだ確認されていません。 以下の点についてご協力いただけますか? 1. 移行手順:MBDT 1.5.0から1.8.0へのモデル移行にはどのような手順が適用されていますか?移行ガイドや変換ユーティリティが利用可能で、直接アップグレードは可能ですか? 2. エラー診断:このget_target_memory_entriesエラーは既知の問題ですか?適用可能なパッチや回避策はありますか? 3. 既存構成:モデルのハードウェア、ターゲットメモリ、またはペリフェラルの設定は変換または再生が必要ですか?もしそうなら、ハードウェア設定が開けない場合、どのように実行すればよいでしょうか? 4. カスタムIOCツールボックス:これらのバージョン間で、カスタムブロックの更新、モデルコールバック、ビルド統合が必要な変更点は?関連するインターフェースと推奨変更点をご確認ください。 5. 診断情報:移行、インストール/パス、カスタムツールボックス統合の問題かを判断するために、どのようなモデルファイル、設定ファイル、ログ、インストールの詳細が必要ですか? 私たちの目標は、既存のIOC機能を維持しつつ、MBDT 1.8.0でモデルを成功裏に設定・構築・実行するために必要な変更を行うことです。 ありがとう。
查看全文
更正 i.MX8DXL EVK (J20) 上 TAMPER_OUT0/TAMPER_IN4 活动防篡改循环的 snvs_cfg 值 您好, 我正在通过 U-Boot 验证 i.MX8DXL EVK (MCIMX8DXL-WEVK) 上的外部主动篡改循环。 根据电路板原理图,我已经确认 J20(防篡改接头,1x3)的接线方式如下: - 引脚 1 = TAMPER_IN4(网络 SNVS.TAMPER_IN4,焊球 AJ13) - 引脚 2 = 接地 - 引脚 3 = TAMPER_OUT0(网络 SNVS.TAMPER_OUT0,引脚 AP22) 这些是专用的 SNVS 引脚,不像 TAMPER_OUT1-4/IN0-3 那样与 SAI2/SAI3 共享。 可用的 U-Boot 命令:tamper_pin_cfg、snvs_cfg(及其子寄存器 hp.lock、hp.secvio_intcfg、hp.secvio_ctl、lp.lock、lp.secvio_ctl、lp.tamper_filt_cfg、lp.tamper_det_cfg、lp.tamper_det_cfg2、lp.tamper_filt1_cfg、lp.tamper_filt2_cfg、lp.act_tamper1_cfg 至 lp.act_tamper5_cfg、lp.act_tamper_ctl、lp.act_tamper_clk_ctl、lp.act_tamper_routing_ctl1、lp.act_tamper_routing_ctl2)、snvs_sec_status、snvs_clear_status。 由于 TAMPER_OUT0/TAMPER_IN4 构成一个有效的防篡改对,我的问题是: 1. lp.act_tamperN_cfg 通道(1-5)中,哪个对应于 TAMPER_OUT0? 2. 要检查 lp.act_tamper_routing_ctl1/routing_ctl2 路由 TAMPER_OUT0 的模式与 TAMPER_IN4 的匹配度,需要检查哪些值? 3. 要使该通道启用模式时钟,lp.act_tamper_clk_ctl 的值是多少? 4. lp.act_tamper_ctl 的全局值是多少才能启用此通道的主动篡改检测? 目标:将跳线连接到 J20 引脚 1-3 时,snvs_sec_status 应显示为安全状态;断开跳线时,应触发违规。 i.MX8DXL 是否有针对外部主动防篡改验证的参考测试程序或应用说明? 谢谢您!
查看全文
about imx6q ddr stresstest I am running a DDR stress test on the i.mX6Q and need to know which Excel file to use. I have obtained `MX6Q_SabreSD_DDR3_register_programming_aid_v2.5.xlsx`; does this appear to be the correct file? I am currently using Samsung K4B4G16 256M×16 chips (4 chips totaling 2GB), but the test fails to complete, returning the error "No chip select is enabled." How can I resolve this issue? Thanks. Re: about imx6q ddr stresstest Hi @GavinChen  This RPA table is right for i.MX6Q. please share your RPA able. B.R
查看全文
RT685 DSPイメージは、MacOS上で新たに組み込まれたZephyr sysbuildの代わりにキャッシュバイナリを使用しています プラットフォーム:MacOS 15.6.1 (24G90) VS Code(バージョン:1.112.0)(ユニバーサル) MCUXpresso for VS Code: 26.8.29 Zephyr toolchain: zephyr-sdk-1.0.1, zsdk nxp-v4.4.1.1 用途: amp_blinkyをZephyr-freestandingとしてインポート 基板: MIMXRT685-EVK 説明: 私はMacOSで開発環境を設定していますが、同じ手順はLinuxマシンでも問題なく動作していました。ビルドとフラッシュは MCUXpressoで重大な警告やエラーを出さなかったが、ARMコアとDSPコアの両方でアプリケーションは正常に動作していた。その後、remote/srcとremote/prj.confのコードを編集し、クリーンビルド後にフラッシュしました。しかし、DSPコアは編集前に前の画像を実行していました。 以下に、興味深い行動例をいくつか示します。 Armコアコードの編集も試みましたが、その変更は成功裏に適用されました。 DSPコアコードの変更は「作業なし」と表示される代わりに、非純粋なビルドを引き起こすことがあります。 cmakeでCCACHEを無効にすると問題が解決するようです。 今のところ、コンパイラがsysbuildを実行する際にDSPイメージの変更を無視し、キャッシュされたバイナリを使っているというCAHCE関連の問題のように思えます。これは再構築されているにもかかわらずです。おそらくnxp_zephyr/zephyr/samples/boards/nxp/adsp/rtxxx/common/src/dspimgsが原因です。Sは更新されていません。また、Linuxマシンでは気づかなかったので、MacOSだけの問題かもしれません。 これは既知の問題ですか?CCACHEを無効にする以外の、より洗練された解決策はありますか? よろしくお願いいたします。 ユエ ゼファー・オス・エッジ  i.MX RT600 Re: RT685 DSP image uses cached binary instead of newly built in Zephyr sysbuild on MacOS こんにちは、シェリーさん。 ご返信ありがとうございます! build/remote/zephyの3つのDSP BINのタイムスタンプ、最終的なArm BIN、そしてdspimgsを確認しました。build/amp_blinky/CMakeFiles/app.dir/.../adsp/rtxxx/common/src/の項目S.obj、すべて純正または非純正のビルドで更新されていました。 また、推奨されている CMake 設定を置き換えて試してみました。 set_source_files_properties ( " ${CMAKE_CURRENT_LIST_DIR} /src/dspimgs.S" オブジェクトに依存する ${HIFI4_BUILD_DIR}/zephyr.elf )   with   設定(HIFI4_BIN_DEPS) 「${HIFI4_BUILD_DIR}/zephyr.elf」 「${HIFI4_BUILD_DIR}/zephyr.reset.bin」 「${HIFI4_BUILD_DIR}/zephyr.text.bin」 「${HIFI4_BUILD_DIR}/zephyr.data.bin」 ) set_source_files_properties ( " ${CMAKE_CURRENT_LIST_DIR} /src/dspimgs.S" プロパティ オブジェクトに依存する " ${HIFI4_BIN_DEPS} " ) dsp-load.cmakeでは、そして変更を検証しました `ninja -C build/amp_blinky -t query build/.../dspimgs.S.obj`   しかし残念ながら、この問題は依然として解決していません。次に、以下のように別のテストを行いました。 remote/src/main.c に` printk ( " TESTCCACHE " );` を追加する ビルド `strings build/.../dspimgs.S.obj | grep TESTCCACHE` を実行します。 呼び出し:'strings build/remote/zephyr/zephyr.text.bin build/remote/zephyr/zephyr.data.bin |grep TESTCCACHE' ステップ3では何も返されなかったが、ステップ4では文字列が見つかった。次に、CCACHEを無効にして再度テストを実行したところ、どちらのテストでもTESTCCACHEが検出されました。CCACHEが有効になっている場合、dspimgs.S.objのタイムスタンプは正しいバイナリをロードせずに更新されたようです。 この件について、ご意見をいただければ幸いです。 よろしくお願いいたします。 ユエ Re: RT685 DSP image uses cached binary instead of newly built in Zephyr sysbuild on MacOS @YueZ様、 ご質問ありがとうございます。 今のところ、私たちの側ではこの問題が既知のものではありません。 根本原因を特定するために、以下の出力が一貫して更新されているか確認していただけますか? リモートビルドプロセスによって生成されるDSP BINです。 dspimgs.S から生成されたオブジェクトファイル。 実際にデバイスにプログラムされている最後のArm BINです。 DSP BINは更新されているが、オブジェクトファイルはdspimgsから生成されていない場合Sは更新していないため、ビルドシステムがDSP BINのタイムスタンプを更新しなかった可能性があります。その結果、依存関係チェックでdspimgs.Sの再コンパイルがスキップされた可能性があります。 DSPIMGsを担当する CMake 構成に以下のコンテンツを追加することをお勧めします。DSP BINの変更が再構築を引き起こすようにするために: セット(DSP_BIN_DIR ${CMAKE_BINARY_DIR}/../リモート/ゼファー) set_properte(ソース ${CMAKE_CURRENT_SOURCE_DIR} /src/dspimgs.S プロパティ オブジェクト_依存 ${DSP_BIN_DIR} /zephyr_reset.bin ${DSP_BIN_DIR} /zephyr_text.bin ${DSP_BIN_DIR} /zephyr_data.bin ) (実際のファイルパスが正しいかどうかも確認してください。) ご質問がありましたら、お気軽にお問い合わせください。   よろしくお願いいたします。 シェリー Re: RT685 DSP image uses cached binary instead of newly built in Zephyr sysbuild on MacOS こんにちは、シェリーさん。 はい、 CCACHE_RECACHE=1は機能します。 ちなみに、CMakeListsでUSE_CCACHEを0に設定してCCACHEを無効にしています。CCACHE_DISABLEについては、動作させるにはwest workspace端末で明示的に設定しなければならず、MCUXpresso for VS Codeを使うにはあまり理想的ではありません。CCACHE_RECACHEも同じで、CMakeListsに追加しても使えません。 よろしくお願いいたします。 ユエ Re: RT685 DSP image uses cached binary instead of newly built in Zephyr sysbuild on MacOS @YueZ様、 CCACHE_RECACHE=1を試してみていただけますか?   ccache を完全にバイパスし、キャッシュエントリの読み書きを行わずに完全な再構築を実行する CCACHE_DISABLE とは異なり、CCACHE_RECACHE=1 はすべての出力の再生成を強制し、新しく構築された結果でキャッシュを更新します。 CCACHE_RECACHE=1 にすることで問題が解消される場合、根本原因はおそらく古いキャッシュの内容にあると考えられます。問題が解決しない場合は、特定のキャッシュされたエントリではなく、ccache自体に問題がある可能性が高いと考えられます。 よろしくお願いいたします。 シェリー  
查看全文
1080p RTSP IPカメラ用のNXP i.MX プロセッサの推奨 こんにちは、皆さん 1080p RTSP IPカメラストリームを処理できる、最も安価なNXP i.MX プロセッサーを誰か教えてもらえますか? 私の要望は以下の通りです。 1つのRTSP IPカメラ入力 2 1080p解像度 3 約25~30 FPS 4 この問題を安定して扱える、最も低コストで i.MX プロセッサ/ボードを探しています 主な目的は、可能な限り低いハードウェアコストで1080pのRTSPカメラストリームを受信し、処理/表示することです。 もし同じようなケースで低コストの i.MX プロセッサを試したことがある方がいれば、ぜひおすすめや体験を共有してください。 よろしくお願いします! Re: Recommendation for NXP i.MX Processor for 1080p RTSP IP Camera こんにちは、 IPカメラを使った純粋な受信・表示アプリケーションとしては、i.MX8MMを検討してください。なぜなら、1080p60デコード対応の専用ハードウェアVPUが含まれているからです。 よろしくお願いいたします。
查看全文
MCXN947 DLL auto-adjusted function not working Hello, I'm using the MCXN947 via FlexSPI with an OctalRAM (IS66WVO32M8DALL-200BLI). The FlexSPI root clock is supplied at 150 MHz via PLL1, and since the RAM operates in DDR mode, I have an output clock rate of 75 MHz. The `flexspi_device_config_t` has the following parameters: flexspi_device_config_t psram_config = { .flexspiRootClk = 150000000U, .isSck2Enabled = false, .flashSize = OCTALRAM_ISSI_SIZE, .CSIntervalUnit = kFLEXSPI_CsIntervalUnit1SckCycle, .CSInterval = 2, .CSHoldTime = 2, .CSSetupTime = 2, .dataValidTime = 2, .columnspace = 4, .enableWordAddress = false, .AWRSeqIndex = HYPERRAM_CMD_LUT_SEQ_IDX_WRITEDATA, .AWRSeqNumber = 1, .ARDSeqIndex = HYPERRAM_CMD_LUT_SEQ_IDX_READDATA, .ARDSeqNumber = 1, .AHBWriteWaitUnit = kFLEXSPI_AhbWriteWaitUnit2AhbCycle, .AHBWriteWaitInterval = 0, .enableWriteMask = true, }; To initialize FlexSpi, I use the SDK FLEXSPI_DRIVER, version 2.6.0. When I configure the delay cells using the auto-adjusted function (as described in the manual under section 10.3.15.6, “DLL configuration for sampling”) with the following values: • SLVDLYTARGET=0x0F (divider 16/32 * root_clock = 3.33 ns) • REFPHASEGAP=0x02 • DLLEN=0x01 • OVRDEN=0x01 After waiting for the ASLVLOCK and AREFLOCK lock bits, I get 0x01 for ASLVSEL and 0x00 for AREFSEL. Consequently, the RAM's read and write functions do not work, since the set delay time is approximately 120 ps! /* Configure DLL. */ configValue = FLEXSPI_CalculateDll(base, config); base->DLLCR[index] = configValue; /* DLL neu kalibrieren */ base->DLLCR[0] |= FLEXSPI_DLLCR_DLLRESET_MASK; base->DLLCR[0] &= ~FLEXSPI_DLLCR_DLLRESET_MASK; /* Exit stop mode. */ base->MCR0 &= ~FLEXSPI_MCR0_MDIS_MASK; /* Lock abwarten */ while ((base->STS2 & (FLEXSPI_STS2_AREFLOCK_MASK | FLEXSPI_STS2_ASLVLOCK_MASK)) != (FLEXSPI_STS2_AREFLOCK_MASK | FLEXSPI_STS2_ASLVLOCK_MASK)) { } SDK_DelayAtLeastUs(10U, CLOCK_GetCoreSysClkFreq()); Even if I use different values for SLVDLYTARGET, the output of ASLVLOCK and AREFLOCK does not change. However, if I set the delay time to a fixed value using the registers OVRDEN=0x01 and OVRDVAL=0x1b (corresponding to a delay time of approximately 3.36 ns), reading from and writing to RAM works without any problems. However, since the root clock is greater than 100 MHz, NXP recommends using the DLL's auto-adjustment feature. Unfortunately, it doesn't seem to be able to determine the correct delay time! Communication & Control(I3C | I2C | SPI | FlexCAN | Ethernet | FlexIO) Core and Memory MCXN Re: MCXN947 DLL auto-adjusted function not working Hi @IbhDaniel  Thank you for the post! The MCXNx4 Reference Manual indicates that the serial root clock is the FlexSPI core clock (see Table 79. Clock Usage). In your case, this clock is configured to 150 MHz. I also see that you have implemented the DLL sampling configuration, and the auto-calibration path appears to be the correct approach. The settings SLVDLYTARGET = 0x0F and DLLEN = 0x01 were configured correctly. The only issue identified was OVRDEN = 0x01 instead of 0x00, which disables the auto-calibration output path and causes ASLVSEL = 0x01 and AREFSEL = 0x00 regardless of the SLVDLYTARGET value. I would just like to confirm that the above analysis applies to your implementation. Could you please verify that: MCR0[RXCLKSRC] = 3h (Flash-memory-provided read strobe and input from DQS pad) is being used in your configuration? Re: MCXN947 DLL auto-adjusted function not working Hi Carlos, Thanks for your reply. Sorry, that was a typo on my part, I set the OVRDEN bit to 0. In the screenshot of the MCU register, you can also see that OVRDEN was set to value 0. I’m using the OctalRam IS66WVO32M8DALL-200BLI, if I understand correctly, this module sends the DQS signal to the MCU. Re: MCXN947 DLL auto-adjusted function not working I checked it again, and the MCR0[RXCLKSRC] bit is set to 3h in the MCU. Re: MCXN947 DLL auto-adjusted function not working Hi @IbhDaniel, Could you please verify that MCR0[RXCLKSRC] = 3h (Flash-memory-provided read strobe input from the DQS pad) is being used in your configuration? This point is important because auto-adjustment/calibration is only supported when the DQS signal is sourced from the external DQS pad. If a different RXCLKSRC setting is selected, the automatic delay adjustment mechanism will not operate as expected.
查看全文
关于 imx6q DDR 压力测试 我正在对 i.mX6Q 进行 DDR 压力测试,需要知道应该使用哪个 Excel 文件。 我已获取到 `MX6Q_SabreSD_DDR3_register_programming_aid_v2.5.xlsx` 文件;请问这是否是正确的文件? 我目前使用的是三星 K4B4G16 256M×16 芯片(4 颗芯片共 2GB),但测试未能完成,并返回错误“未启用芯片选择”。 我该如何解决这个问题? 谢谢。 Re: about imx6q ddr stresstest 嗨@GavinChen 此 RPA 表适用于 i.MX6Q。 请分享您的RPA能力。 B.R
查看全文