Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
HSE Firmware Installation luojing_0-1782185681956.png Where can I download the HSE-B Firmware Reference Manual document as shown in the above figure? Please provide a download link.Thanks. Re: HSE Firmware Installation Hi luojing, If you have already signed an NDA, please refer to the steps in the document to register and upload your NDA. https://www.nxp.com.cn/docs/en/user-guide/nxp-secure-access-rights-registration.pdf Then you will see RM00286 HSE-B Firmware Reference Manual - V2.7. download RM00286 HSE-B Firmware Reference Manual - V2.7 Secure File.png Best Regards, Robin
View full article
MCXA174:J-FLASH device list has no MCXA174/3 DEVICE, cannot erase\read\program, how to fix it? I am currently using the MCXA174 chip and need to program code with J-Link. However, when creating a project in J-Flash and reaching the device selection step, there is no available option for the MCXA174/3 chip. I have tried selecting MCXA15X and MCXA344 as alternative devices, but none of them worked. What should I do? Thank you. SEGGER JLINK Software version V9.52 dylan_yu_0-1782201264463.png MCXA Re: MCXA174:J-FLASH device list has no MCXA174/3 DEVICE, cannot erase\read\program, how to fix it? I only have a j-link, which is a general-purpose burner. Is there any other way to use it? Can NXP provide the necessary files to add the device, such as .xml, .jlinkscript, and .FLM files? If not, it would be too unfriendly to users. Re: MCXA174:J-FLASH device list has no MCXA174/3 DEVICE, cannot erase\read\program, how to fix it? Hello NXP does not control for when third-party tool vendors add support for specific devices to their development environments; As of the release notes for most recent versions on the tool page, the MCXA174/3 is not listed yet. If you want to program the MCXA174, you could use debuggers from NXP as the MCU Link. Let me know if you need more information on this Best Regards Re: MCXA174:J-FLASH device list has no MCXA174/3 DEVICE, cannot erase\read\program, how to fix it? Hello, I would recommend checking with Segger support to verify a launching version for the support on this device. Additional, I found some links from Segger page that could be helpful for you. J-Link Device Support Kit - SEGGER Knowledge Base Has a section on adding new devices NXP MCX A - SEGGER Knowledge Base has the MCXA family information including MCXA174 Best Regards.
View full article
Verfiying Backdoor access key using in S32k144 Before project start i wanna verfity backdoor test using s32k144. I have a example code about unsecureProject. (Example_S32K144_Verify_Backdoor_Access_Key_S32DS1.3_v2.zip) compare with example code and Referenece manual I have some question. 1. According to the Reference Manual about Verify Backdoor Access Key, it states like below table. LGI_0-1782174796203.png FCCOB Number 0 is used when command. but in the code, FCCOB Number 4 is used when command. LGI_1-1782174829617.png so I wondered. FTFC->FCCOB[0x0] = 0x45; // Backdoor Key Verify command (0x45) FTFC->FCCOB[0x3] = 0x45; // Backdoor Key Verify command (0x45) which is the right one? 2. I want to check the lock and unlock(verify backdoor access) mechanism. First. Set the backdoor key using T32. (I know it isn't normal way. usually insert the code)        ex)  Data.Set SD:0x400 %LE %Long &pwd_Head                  Data.Set SD:0x404 %LE %Long &pwd_Tail               Data.Set SD:0x40C %LE %Long 0xFFFF7FBF Second. upon reset, the FSEC register (0x40020002) is initialized with the value stored in the security byte of the Flash Configuration Field (0x40C).       Q. 2-1. Does this mean the device remains in the unsecure state until reset, and after reset, the FSEC register (0x40020002) is updated with the value read from 0x40C, causing the device to enter the secure state? LGI_2-1782175329362.png Third. When Verify Backdoor Access, Reference Manual mention like capture below. LGI_3-1782175422077.png Q. 2-2. Does this mean the FSEC register is temporarily changed to the unsecured mode and then restored after reset? On reset,  FSEC register (0x40020002) read value from 0x40C again right? Q. 2-3. When this update occurs, is only the security-related bit changed, or is the entire FSEC byte overwritten? For example, is the transition BF → FE or BF → BE? 3. Based on this description, once the keys do not match, the device remains secured until reset. In this situation, if backdoor access is disabled, how can the device be reset? LGI_4-1782176250749.png 4. When I execute the following command: Data.Set AD:0x40020000 %Byte 0x30 and then immediately read it back using: Data.Byte(AD:0x40020000) the value still remains 0x80. What could be the reason for this behavior, and what does it mean? ================================================================== So, I think When programming data into the S32K144, the configuration values are written to the 0x400–0x40F region. When the MCU is reset or rebooted, the FTFC registers read the configuration values stored in the 0x400–0x40F region and operate according to those settings.       right? Also, the backdoor comparison key appears in startup_S32K144.S, should I understand that the configuration is applied before entering main()? ================================================= Using the address 0x40000100 or 0x40000104 to check the unsecure status. Is this correct? I could not find any related description in the Reference Manual. thank you.  #s32k144 @backdoor access Re: Verfiying Backdoor access key using in S32k144 thank you for your support!! Re: Verfiying Backdoor access key using in S32k144 Hi @LGI, A4 follow up: At address 0x40020000, the FSTAT register is located. As mentioned previously, this register cannot be written in a way that sets bits from 0 to 1. Writing a ‘1’ to a bit only clears it (W1C – Write‑1‑to‑Clear). Therefore, writing ‘1’ does not set a bit; it only clears bits that are already ‘1’. A8 follow up: These are the MDM‑AP status and control registers, which are accessible only through the Arm Debug Access Port (DAP). For example, it is used in this script: https://community.nxp.com/t5/S32K-Knowledge-Base/Lauterbach-Script-For-MDM-AP-Mass-erase-S32K142/ta-p/2336449 Regards, Daniel Re: Verfiying Backdoor access key using in S32k144 thank you for your answer. @danielmartynek  then, I have some question for your answer.  A4. I wrote 0x30 to address 0x40020000, but when I read it back, the value did not change to 0x30 and remained 0x80. What could be the reason for this behavior, and what does it mean? Q8. This is actually related to a Trace32 example. In the Trace32 example for the S32K144, addresses 0x40000100 and 0x40000104 are used for security state information. However, I could not find any information about addresses 0x40000100 and 0x40000104. That’s the point I’m asking about. Thank you for your support. Re: Verfiying Backdoor access key using in S32k144 Hi @LGI, A1: It is FTFC->FCCOB[0x3] = 0x45; // Backdoor Key Verify command (0x45) Because FCCOB0 is the 4th register in the memory map. danielmartynek_0-1782199747739.png A2: You can program the Flash Configuration Field using a programmer/debugger, but the sector must be erased beforehand. Note that a mass erase also programs the FSEC byte to the Unsecure state. A2.1: Yes A2.2: Yes A2.3: Only FSEC[SEC]. A3: There are many reset sources on the MCU (RM, 25.2.2 System reset sources). The debugger can reset the MCU by asserting Reset_b pin (PTA5). A4: Write to the register has the W1C function only: danielmartynek_1-1782200487390.png Q5: When programming data into the S32K144, the configuration values are written to the 0x400–0x40F region. A5: Yes Q6: When the MCU is reset or rebooted, the FTFC registers read the configuration values stored in the 0x400–0x40F region and operate according to those settings. A6: Yes, the MCU loads the FTFC registers with the values in the Flash configuration field. Q7: Also, the backdoor comparison key appears in startup_S32K144.S, should I understand that the configuration is applied before entering main() A7: Reset is required, but this is what the programmer/debugger usually does after programming. Q8: Using the address 0x40000100 or 0x40000104 to check the unsecure status. Is this correct? A9: I'm not what you mean. Please elaborate. Regards, Daniel
View full article
我想在 Yocto 上运行 Qt 应用程序,并使用 Wayland 作为后端。 我想在 基于 iMX9332 + Linux 6.12.49 和从 imx-image-full-imx93evk.wic 中提取的 rootfs 的 wayland 后端上 运行 Qt 应用程序 。 但发生错误:qt.qpa.wayland:qtvirtualkeyboard 目前在客户端不受支持,请在合成器端使用 QT_IM_MODULES=qtvirtualkeyboard。 如何使用 QT qtvirtualkeyboard? 谢谢! Yocto Project Re: I want to run Qt Application on Yocto with wayland backend. 你好@OscarLi 希望你一切都好。 imx-image-full图像默认使用 Weston 作为 Wayland 合成器。 Weston 通过 weston.ini 处理输入法。位于 /etc/xdg/weston/weston.ini。 在该文件中,您需要添加 [input-method] 并设置 QT 虚拟键盘框架。 例如: [input-method] path=/usr/libexec/qtvirtualkeyboard-path 然后导出: export QT_IM_MODULE=qtvirtualkeyboard ./your-qt-application -platform wayland 您也可以尝试: export QT_IM_MODULE=wayland ./your-qt-application -platform wayland 顺祝商祺! 萨拉斯。
View full article
NFC CSV Import Error, why? HTTPS URLS We purchased NTAG215 tags specifically because they support up to 540 bytes of NDEF data. We spent more than 200 EUR on these tags to ensure that our long verification URLs would fit without any issues. However, the NXP TagWriter app refuses to import our CSV file and always reports “Invalid format”. The CSV structure is correct (RecordType,URI), the file is saved as UTF-8 with BOM, the URLs are valid, and the tags have enough memory. The same data can be written manually to a single tag without any problem. The issue only happens during CSV import. This means the limitation is not the tag, not the URL, and not the CSV format. The limitation appears to be inside the TagWriter app itself. It is extremely frustrating that after spending this amount of money on official NXP tags, we cannot use the official NXP app to batch-write them. We should not be forced to buy a third-party app just to perform a basic operation that TagWriter claims to support. We need clarification on the following points: Why does TagWriter reject valid CSV files when the URL length is within the NTAG215 memory limits? Is this a known limitation or a bug in the CSV import function? Is there an official workaround that does not require paying for another app? We urgently need a solution, because we purchased these tags specifically for this use case. Re: NFC CSV Import Error, why? HTTPS URLS and my URL is looking like this: https://200.410.222.111:4443/verify-status.html?work_id=9d611323a-a9ac-4fb9-9039-74f443cf2720&sig=MKIRQDMQl3/NKQXSKLwZ123IvEgxkda123Gq0LOPqBz84mQIhANGc2GQFSNONSWR27nps0NMieAF5rZSkXt2j2rgquKh6 Re: NFC CSV Import Error, why? HTTPS URLS thank you, but now he shows nothing. No error but also no data. It looks lik this for testing - normal case we have much longer URL Re: NFC CSV Import Error, why? HTTPS URLS Hello sir, I was checking your CSV file, there are some fields that you need to add to your structure. Please refer to the following community case: Error "Not valid NDEF records found" when trying to select a CSV in TagWriter for Android - NXP Community In the User Manual, please check the description of 3) LINK_RECORD. Have a great day, sir! Re: NFC CSV Import Error, why? HTTPS URLS Hello, Could you please confirm whether you are able to successfully read a short link from the NDEF? I ask because, if this is working, it is very likely that the issue lies in the NDEF structure itself. Please note that, according to the NFC Forum specification, there are both Records and Short Records. If your payload size exceeds 255 octets, it is possible that the NDEF has not been constructed correctly. I recommend reviewing the NFC Data Exchange Format specification available on the NFC Forum website.
View full article
MCXA174:J-FLASH 设备列表中没有 MCXA174/3 设备,无法擦除/读取/编程,如何解决? 我目前正在使用MCXA174芯片,需要使用J-Link进行编程。但是,在 J-Flash 中创建项目并到达设备选择步骤时,没有 MCXA174/3 芯片的可用选项。我尝试选择 MCXA15X 和 MCXA344 作为备选设备,但它们都无法正常工作。我应该怎么办?谢谢。 SEGGER JLINK 软件版本 V9.52 dylan_yu_0-1782201264463.png MCXA Re: MCXA174:J-FLASH device list has no MCXA174/3 DEVICE, cannot erase\read\program, how to fix it? 我只有一台 J-Link 烧录器,它是一款通用型烧录器。还有其他使用方法吗?NXP能否提供添加该设备所需的必要文件,例如.xml文件?.jlinkscript,还有.FLM文件?否则,对用户来说就太不友好了。 Re: MCXA174:J-FLASH device list has no MCXA174/3 DEVICE, cannot erase\read\program, how to fix it? Hello NXP 无法控制第三方工具供应商何时将对特定设备的支持添加到其开发环境中;根据工具页面上最新版本的版本说明,MCXA174/3 尚未列出。 如果要对 MCXA174 进行编程,可以使用 NXP 的调试器作为 MCU Link。 如果您需要更多相关信息,请告诉我。 顺祝商祺! Re: MCXA174:J-FLASH device list has no MCXA174/3 DEVICE, cannot erase\read\program, how to fix it? 你好, 我建议您联系 Segger 技术支持,确认该设备支持的启动版本。 另外,我在Segger的页面上找到了一些可能对您有帮助的链接。 J-Link 设备支持套件 - SEGGER 知识库包含有关添加新设备的章节 NXP MCX A - SEGGER 知识库包含 MCXA 系列产品信息,包括 MCXA174。 顺祝商祺!
View full article
Yocto上でWaylandのバックエンドでQtアプリケーションを実行したいです。 iMX9332 + Linux 6.12.49上でWaylandバックエンドベースでQt アプリケーションを実行し、imx-image-full-imx93evk.wicから抽出したrootfs を使いた い です。 しかし、エラーが発生しました: qt.qpa.wayland:現在、qtvirtualkeyboard はクライアント側ではサポートされていません。コンポジタ側で QT_IM_MODULES=qtvirtualkeyboard を使用してください。 QTのqtvirtualkeyboardの使い方は? ありがとう! Yocto Project Re: I want to run Qt Application on Yocto with wayland backend. こんにちは、 @OscarLi お元気でお過ごしのことと思います。 imx-image-fullイメージは、デフォルトのWaylandコンポジタとしてWestonを使用します。 ウェストンは入力方法をweston.iniで扱います。/etc/xdg/weston/weston.ini にあります。 そのファイルで[input-method]を追加し、QT仮想キーボードフレームワークを設定する必要があります。 例えばこんな感じです。 [input-method] path=/usr/libexec/qtvirtualkeyboard-path 次に、エクスポートします。 export QT_IM_MODULE=qtvirtualkeyboard ./your-qt-application -platform wayland また、以下も試してみることができます: export QT_IM_MODULE=wayland ./your-qt-application -platform wayland よろしくお願いいたします。 サラス。
View full article
NFC CSV 导入错误,为什么?HTTPS URL 我们特意购买了 NTAG215 标签,因为它们支持高达 540 字节的 NDEF 数据。我们花费了超过 200 欧元购买这些标签,以确保我们较长的验证 URL 能够顺利显示。 但是,NXP TagWriter 应用程序拒绝导入我们的 CSV 文件,并始终报告“格式无效”。CSV 结构正确(记录类型,URI),文件以带 BOM 的 UTF-8 格式保存,URL 有效,标签有足够的内存。同样的数据可以手动写入单个标签,不会有任何问题。该问题仅在导入 CSV 文件时出现。 这意味着限制因素不是标签、URL 或 CSV 格式。该限制似乎出在 TagWriter 应用程序本身。 令人极其沮丧的是,我们花了这么多钱购买了官方的 NXP 标签,却无法使用官方的 NXP 应用程序批量写入它们。我们不应该被迫购买第三方应用程序才能执行 TagWriter 声称支持的基本操作。 我们需要澄清以下几点: 为什么当 URL 长度在 NTAG215 内存限制范围内时,TagWriter 会拒绝有效的 CSV 文件? 这是已知的限制还是 CSV 导入功能中的一个漏洞? 是否有无需付费购买其他应用程序的官方解决方法? 我们急需一个解决方案,因为我们购买这些标签就是为了应对这种情况。 Re: NFC CSV Import Error, why? HTTPS URLS 我的网址看起来像这样: https://200.410.222.111:4443/verify-status.html?work_id=9d611323a-a9ac-4fb9-9039-74f443cf2720&sig=MKIRQDMQl3/NKQXSKLwZ123IvEgxkda123Gq0LOPqBz84mQIhANGc2GQFSNONSWR27nps0NMieAF5rZSkXt2j2rgquKh6 Re: NFC CSV Import Error, why? HTTPS URLS 谢谢,但他现在什么也不显示了。没有错误提示,但也没有数据。测试时看起来是这样的——正常情况下我们的URL要长得多。 Re: NFC CSV Import Error, why? HTTPS URLS 您好,先生, 我查看了您的 CSV 文件,发现您需要在结构中添加一些字段。 请参考以下社区案例:尝试在 TagWriter for Android 中选择 CSV 文件时出现“未找到有效的 NDEF 记录”错误 - NXP 社区 请在用户手册中查看 3) LINK_RECORD 的描述。 祝您今天过得愉快,先生! Re: NFC CSV Import Error, why? HTTPS URLS 你好, 请问您是否能够成功读取 NDEF 发送的短链接? 我这样问是因为,如果这样可以正常工作,那么问题很可能出在 NDEF 结构本身。请注意,根据 NFC 论坛规范,既有记录也有短记录。如果您的有效载荷大小超过 255 字节,则 NDEF 可能未正确构造。 我建议您查阅 NFC 论坛网站上提供的 NFC 数据交换格式规范。
View full article
FS32K144UAT0VLLT(RESET)のピン97(PTA5)で三角波レベルが観測されました。 マネージャー: FS32K144UAT0VLLT回路は、5VDC電源、20MHz外部水晶発振器、および10pF整合コンデンサを使用します。外部水晶発振器が発振を開始せず、ホストコンピュータはソフトウェアを使用してこのチップに正常に接続できません。 この32K144UAチップの97番ピンでPTA5(リセット)レベルを測定したところ、周波数1280Hz、振幅3.3Vp-pの三角波が検出された。 下の画像に示すように、原因の分析にご協力をお願いします。LDO電源チップは5Vで正常に動作しているのに、なぜ水晶発振器が発振しないのでしょうか?リセットピンが三角波を生成するのはなぜでしょうか?はんだ付け不良はどこが原因でしょうか?よろしくお願いいたします。 FS32K144UAT0VLLT第97脚PTA5(RESET)电平.jpg Re: FS32K144UAT0VLLT第97脚PTA5(RESET)出现三角波电平 こんにちは リセットピンは現在コンデンサに接続されているため、三角波が表示されています。まずコンデンサを取り外してリセットピンの波形を確認するか、 S32K1xxシリーズMCUアプリケーションガイドのセクション7「S32K1xxシリーズMCUにおけるロックアップリセットの原因分析と復旧方法」を参照して、具体的な状況を確認してください。 リセットピンは定期的にローレベルに引き下げられ、プログラムが実行されないため、水晶発振器はプログラム内のイネーブルビットに従って発振を開始できません。 以前VDDが3.3Vで動作していたチップで、VREFHが5Vで動作している場合は、そのチップをテストしないでください。チップを再はんだ付けしてから、デバッガを使用してプログラムをダウンロードすることをお勧めします。 よろしくお願いします、 ロビン 回复: FS32K144UAT0VLLT第97脚PTA5(RESET)出现三角波电平 先生方へ: 補充する: 上記のFS32K144UAT0VLLTのリセット回路は、リセットピンに10KΩの抵抗を接続して+5Vにプルアップし、100nFのコンデンサをGNDに接続しています。ありがとうございました! Re: FS32K144UAT0VLLT第97脚PTA5(RESET)出现三角波电平 マネージャー: リセット回路からコンデンサを取り外すと、図に示すようにパルスが発生します。 1. 「 7. S32K1xxシリーズMCUチップのロックアップの解析と復旧方法」を参照。J-llnkはコンピュータに正常に接続できませんが、ST-linkは接続できますが、ソフトウェアがそれをサポートしていません。 2. リセット回路がJ-Linkに正しく接続できません。接続時にリセット回路にコンデンサをはんだ付けする必要があるのでしょうか?現在、リセット回路には5Vへの10kΩプルアップ抵抗、5V電源、GNDに接続された100nFコンデンサがありますが、それでもJ-Linkに接続できません。どのような対策を講じるべきでしょうか? 3. FS32K144UAT0VLLTは新品で、既に2個交換済みです。新しいチップでも暗号化の問題が発生するのはなぜですか? ありがとう! 复位电路去掉电容后.jpg Re: FS32K144UAT0VLLT第97脚PTA5(RESET)出现三角波电平 リセットピンの波形は以下と一致しているようです。 ② RESETピンは周期的なリセットパルス信号を出力します。 a. リセット信号の周期が約118µsで、ハイレベル時間が約660nsの場合、それは方形波信号です。 SWD/JTAGデバッグインターフェースを介して一括消去コマンドを実行することで、MCUの暗号化を解除し、データを復元することができます。 この記事に記載されているBaidu Cloud Driveのリンクにあるスクリプトを使用することをお勧めします。 Re: FS32K144UAT0VLLT第97脚PTA5(RESET)出现三角波电平 Robin_Shen: この回路は5Vで動作し、リセット回路には5Vへの10kΩのプルアップ抵抗が接続されています。接地コンデンサは接続されていません。接続時に接地コンデンサを追加する必要がありますか? J-Linkで「unlock kinetis」コマンドを入力したところ、コンピュータは次のように応答しました。 デバイスのロック解除中...エラー: DP/APレジスタからの読み取りに失敗しました! 1. リセットピンのパルス波形は下図に示されており、周期は約118µsです。 PNG_20266257220.png 2. パルス全体の持続時間は1500 nsです。FS32K144が5Vで動作する場合、ハイレベルリセットのしきい値はどれくらいですか? 下の図のハイレベル持続時間は660 nsですか? 下の図のハイレベル持続時間は許容範囲内ですか? PNG_20266256505.png 3. J-Link> の下にコマンドを入力し、スクリーンショットを撮ります。 (1)J-Link>で「connect」と入力し、応答に「?」と入力します。FS32K144UAT0VLLTを使用してS32K144(ALLOW SECURITY)を選択しますが、これでよろしいでしょうか?下図を参照してください。 选择.png (2)周波数が112000kHzの場合、適切なオプションが表示されません。ここに周波数を入力するにはどうすればよいですか? 选择2.png (3)以下は、J-LinkでCommandやUnlock Kinetisなどのコマンドを入力した際の応答のスクリーンショットです。入力ミスがないかご確認ください。よろしくお願いいたします。 1.png 2.png Re: FS32K144UAT0VLLT第97脚PTA5(RESET)出现三角波电平 1でも2でもどちらでも構いません。 3(1) 開発段階では、「セキュリティを許可する」を選択しないことをお勧めします(これはWeChatの記事で説明されているので、よく読んでください)。 3(2) チップはFS32K144UAT0VLLTですが、スクリーンショットのデバイスにS32K11シリーズを選んだのはなぜですか?また、112000KHZという周波数が何を意味するのか分かりません。SWDまたはJTAGのレートを低くすることもできます。 3(3) 5Vで動作するとおっしゃっていませんでしたか?なぜVTref=3.309Vなのでしょうか?デバッグインターフェースがAN5426の「表8. S32K1xx - JTAGおよびSWDインターフェース」および「図11」に準拠しているかどうか教えてください。「JTAG/SWD信号接続」について。もしくは、回路図の最小限の部分を送っていただければ、私が確認します。 また、S32K144に電力を供給するLDOは、少なくとも250mAを供給する必要があることに注意してください(詳細はERR052094を参照)。 Re: FS32K144UAT0VLLT第97脚PTA5(RESET)出现三角波电平 Robin_Shen: こんにちは、先生: 1. J-Linkで「unlock kinetis」コマンドを入力すると、以下の応答が表示されます。 11.png これはつまり、ロック解除に成功したということですよね? 2. しかし、PTA5リセットピンを測定すると、依然として三角波が得られます。 222.png 3. 回路基板とホストコンピュータのダウンロードソフトウェアが接続されたとき、カーネルを表示している下の画像に示すように、リセットピンのレベルは直線状の4Vラインである必要があります。 下のウィンドウが閉じられると、リセットピンの波形が再び三角波に変わります。これは正常な動作でしょうか? さらに、チップのロックを解除した後、SWDIO接続を行う際にはリセット信号線を追加する必要があります。そうしないと接続できません。これはなぜでしょうか? ありがとう! 33.png Re: FS32K144UAT0VLLT第97脚PTA5(RESET)出现三角波电平 1. はい。その後、リセットピンがハイレベルに戻るように、プログラムをチップにダウンロードする必要があります。 2. WeChatの記事によると、フラッシュメモリにコードがない場合(例えば、フラッシュメモリが空の新しいチップの場合)、コアロックアップによりMCUは定期的にリセットされ続けるとのことです。このことから、空のチップのリセットピンにコンデンサを接続すると三角波が観測され、コンデンサを接続しないと周期的なパルスが観測される理由が説明できます。 3. 接続、リセット、ダウンロード、またはプログラミング処理中は、通常CPUは停止します。一度停止すると、CPUはリセットされません。しかし、なぜリセットレベルは4Vしかないのでしょうか?デバッグインターフェース回路が正しいかどうか、再度確認させてください。 Table 8. S32K1xx - JTAG and SWD interface AN5426.png S32K1のリセット信号をデバッガのリセット信号に接続する必要があります。
View full article
使用 S32k144 验证后门访问密钥 在项目开始之前,我想使用 s32k144 进行后门测试验证。 我有一个关于 unsecureProject 的示例代码。(示例_S32K144_验证后门访问密钥_S32DS1.3_v2.zip) 与示例代码和参考手册对比后,我有一些疑问。 1.根据《验证后门访问密钥参考手册》,其内容如下表所示。 LGI_0-1782174796203.png FCCOB 编号 0 用于执行命令。 但在代码中,当发出命令时,会使用 FCCOB 编号 4。 LGI_1-1782174829617.png 所以我很好奇。 FTFC->FCCOB[0x0] = 0x45; // 后门密钥验证命令 (0x45) FTFC->FCCOB[0x3] = 0x45; // 后门密钥验证命令 (0x45) 哪个才是正确的? 2. 我想检查锁定和解锁(验证后门访问权限)机制。 第一的。使用 T32 设置后门钥匙。(我知道这不是正常的方式。)通常插入代码) 例如) Data.Set SD:0x400 %LE %Long &pwd_Head 数据集 SD:0x404 %LE %Long &pwd_Tail 数据集 SD:0x40C %LE %Long 0xFFFF7FBF 第二。upon RESET, the FSEC register (0x40020002) is initialized with the value stored in the security 字节 of the Flash Configuration Field (0x40C). 问:2-1。这是否意味着设备在 RESET 前一直处于不安全状态,RESET 后,FSEC 寄存器 (0x40020002) 会更新为从 0x40C 读取的值,从而使设备进入安全状态? LGI_2-1782175329362.png 第三。验证后门访问权限时,参考手册中提到如下截图所示。 LGI_3-1782175422077.png Q. 2-2.这是否意味着 FSEC 寄存器会暂时更改为非安全模式,然后在 RESET 后恢复?On RESET, FSEC 寄存器 (0x40020002) 会再次从 0x40C 读取值,对吗? 问题 2-3。发生此更新时,是否仅更改与网络安全相关的位,还是会覆盖整个 FSEC 字节? 例如,转变是 BF → FE 还是 BF → BE? 3. 根据此描述,一旦密钥不匹配,设备将保持安全状态,直到 RESET 为止。在这种情况下,如果后门访问被禁用,如何重置设备? LGI_4-1782176250749.png 4. 当我执行以下命令时: 数据集 AD:0x40020000 %字节 0x30 然后立即使用以下命令将其读出: Data.Byte(AD:0x40020000) 该值仍然为 0x80。 这种行为背后的原因是什么?它又意味着什么? ================================================================== 所以,我认为 当向 S32K144 中编程数据时,配置值被写入 0x400–0x40F 区域。 当 MCU 复位或重启时,FTFC 寄存器会读取存储在 0x400–0x40F 区域中的配置值,并根据这些设置进行操作。 正确的? 另外,后门比较密钥出现在 startup_S32K144.S 中,我是否应该理解为该配置是在进入 main() 之前应用的? ================================================= 使用地址 0x40000100 或 0x40000104 检查不安全状态。 是这样吗? 我在参考手册中找不到任何相关描述。 谢谢。 #s32k144 @后门访问 Re: Verfiying Backdoor access key using in S32k144 感谢您的支持! Re: Verfiying Backdoor access key using in S32k144 嗨@LGI , A4后续报道: FSTAT 寄存器位于地址 0x40020000。 如前所述,该寄存器不能以将位设置为 0 到 1 的方式写入。 向位写入“1”只会清除该位(W1C – Write‑1‑to‑Clear)。因此,写入“1”并不会设置一个位;它只会清除已经为“1”的位。 A8后续报道: 这些是 MDM-AP 状态和控制寄存器,只能通过 Arm 调试访问端口 (DAP) 访问。 例如,它在以下脚本中被使用: https://community.nxp.com/t5/S32K-Knowledge-Base/Lauterbach-Script-For-MDM-AP-Mass-erase-S32K142/ta-p/2336449 此致, 丹尼尔 Re: Verfiying Backdoor access key using in S32k144 谢谢你的回答。@danielmartynek 那么,我有一些问题想请教您。 A4。我向地址 0x40020000 写入了 0x30,但是当我读回它时,该值没有变为 0x30,而是保持为 0x80。 这种行为背后的原因是什么?它又意味着什么? Q8.这实际上与 Trace32 示例有关。 在 S32K144 的 Trace32 示例中,地址 0x40000100 和 0x40000104 用于安全状态信息。 但是,我找不到有关地址 0x40000100 和 0x40000104 的任何信息。这就是我问的重点。 感谢您的支持。 Re: Verfiying Backdoor access key using in S32k144 嗨@LGI , A1: 它是 FTFC->FCCOB[0x3] = 0x45; // 后门密钥验证命令 (0x45) 因为 FCCOB0 是内存映射中的第 4 个寄存器。 danielmartynek_0-1782199747739.png A2:您可以使用编程器/调试器对 Flash 配置字段进行编程,但必须事先擦除该扇区。请注意,批量擦除还会将 FSEC 字节编程为不安全状态。 A2.1:是 A2.2:是 A2.3:仅限 FSEC[SEC]。 A3:MCU 上有许多 RESET 源(RM,25.2.2 系统 RESET 源)。 调试器可以通过置位 Reset_b 引脚 (PTA5) 来重置 MCU。 A4:写入寄存器仅具有 W1C 功能: danielmartynek_1-1782200487390.png Q5:当向 S32K144 中编程数据时,配置值写入 0x400–0x40F 区域。 A5:是的 Q6:当MCU复位或重启时,FTFC寄存器读取存储在0x400–0x40F区域中的配置值,并根据这些设置进行操作。 A6:是的,MCU 会将 Flash 配置字段中的值加载到 FTFC 寄存器中。 Q7:另外,后门比较密钥出现在 startup_S32K144.S 中,我是否应该理解为该配置是在进入 main() 函数之前应用的? A7:RESET是必需的,但这是编程人员/调试人员在编程后通常会执行的操作。 Q8:使用地址 0x40000100 或 0x40000104 检查不安全状态。这样对吗? A9:我不是你指的那种人。请详细说明。 此致, 丹尼尔
View full article
HSE固件安装 luojing_0-1782185681956.png 我可以在哪里下载如上图所示的 HSE-B 固件参考手册文档?请提供下载链接。谢谢。 Re: HSE Firmware Installation 罗静你好, 如果您已经签署了保密协议,请参考文档中的步骤进行注册并上传您的保密协议。https://www.nxp.com.cn/docs/en/user-guide/nxp-secure-access-rights-registration.pdf 然后您将看到RM00286 HSE-B 固件参考手册 - V2.7 。 download RM00286 HSE-B Firmware Reference Manual - V2.7 Secure File.png 此致敬礼, Robin
View full article
A triangular waveform level was observed at pin 97 (PTA5) of the FS32K144UAT0VLLT (RESET). manager: The FS32K144UAT0VLLT circuit uses a 5VDC power supply, a 20MHz external crystal oscillator, and a 10pF matching capacitor. The external crystal oscillator does not start oscillating, and the host computer cannot connect to this chip normally using SW. Measuring the PTA5 (RESET) level at pin 97 of this 32K144UA chip revealed a triangular wave with a frequency of 1280Hz and an amplitude of 3.3Vp-p. As shown in the image below, please help me analyze the cause. The LDO power supply chip is working normally with 5V, so why is the crystal oscillator not oscillating? How can the reset pin generate a triangular wave? Where is the poor soldering causing this? Thank you! FS32K144UAT0VLLT第97脚PTA5(RESET)电平.jpg Re: FS32K144UAT0VLLT第97脚PTA5(RESET)出现三角波电平 Hi The reset pin is currently connected to a capacitor, causing it to display a triangular wave. You can either remove the capacitor first and observe the reset pin waveform, or refer to section 7, " Analysis of Causes and Recovery Methods for Lockup Resets in S32K1xx Series MCUs," in the S32K1xx Series MCU Application Guide to determine the specific situation. The reset pin is periodically pulled low, and the program does not start running, so the crystal oscillator cannot start oscillating according to the enable bit in the program. Do not test the chip that was previously powered by VDD 3.3V but VREFH is powered by 5V. It is recommended to resolder a chip and then use a debugger to download the program. Best Regards, Robin 回复: FS32K144UAT0VLLT第97脚PTA5(RESET)出现三角波电平 Dear teachers: Replenish: The reset circuit for the FS32K144UAT0VLLT above has a 10K resistor connected to the reset pin to pull it up to +5V, and a 100nF capacitor connected to GND. Thank you! Re: FS32K144UAT0VLLT第97脚PTA5(RESET)出现三角波电平 The reset pin waveform appears to match: ② The RESET pin outputs a periodic reset pulse signal. a. If the reset signal period is ~118µs and the high-level time is ~660ns, it is a square wave signal. The MCU can be decrypted and recovered by executing the mass erase command through the SWD/JTAG debug interface. I suggest using the script in the Baidu Cloud Drive link provided in this article. Re: FS32K144UAT0VLLT第97脚PTA5(RESET)出现三角波电平 manager: After removing the capacitor from the reset circuit, it generates a pulse, as shown in the figure. 1. Referring to " 7. Analysis and Recovery Methods for Lockup of S32K1xx Series MCU Chips", J-llnk cannot connect to the computer normally, but ST-link can, but the software does not support it; 2. The reset circuit cannot connect to the J-Link properly. Does the reset circuit need to be soldered with a capacitor during connection? Currently, the reset circuit has a 10k pull-up to 5V, a 5V power supply, and a 100nF capacitor connected to GND, but it still cannot connect to the J-Link. What measures should be taken? 3. The FS32K144UAT0VLLT is new, and two have already been replaced. Why is the encryption issue occurring even with the new chip? Thanks! 复位电路去掉电容后.jpg Re: FS32K144UAT0VLLT第97脚PTA5(RESET)出现三角波电平 Robin_Shen: The circuit is powered by 5V, and the reset circuit has a 10K pull-up resistor to 5V. There is no grounding capacitor. Is it necessary to add a grounding capacitor when connecting? After entering the command "unlock kinetis" in J-Link, the computer responded as follows: Unlocking device...ERROR: Read from DP/AP register failed! 1. The reset pin pulse waveform is shown in the figure below, with a period of approximately 118µs. PNG_20266257220.png 2. The entire pulse duration is 1500 ns. If the FS32K144 operates at 5V, what is the high-level reset threshold? Is the high-level duration in the diagram below 660 ns? Is the high-level duration in the diagram below acceptable? PNG_20266256505.png 3. Enter the command under J-Link> and take a screenshot: (1) Enter "connect" under J-Link>, and enter "?" in the reply. Select S32K144 (ALLOW SECURITY) using FS32K144UAT0VLLT, is that correct? See the figure below: 选择.png (2) When the frequency is 112000KHZ, no suitable options appear. How should the frequency be entered here? 选择2.png (3) Below are screenshots of the responses when entering commands such as Command and Unlock Kinetis in J-Link. Please check where the input is incorrect, thank you! 1.png 2.png Re: FS32K144UAT0VLLT第97脚PTA5(RESET)出现三角波电平 Either 1 or 2 is fine. 3(1) During the development phase, it is recommended not to select "allow security" (this is explained in WeChat articles, so please read them carefully). 3(2) Your chip is FS32K144UAT0VLLT, but why did you choose the S32K11 series for the Device in the screenshot? I don't understand what frequency 112000KHZ you mentioned is. You can choose a lower SWD or JTAG rate. 3(3) Didn't you say it's powered by 5V? How come VTref=3.309V? Please tell me if the debugging interface conforms to AN5426's "Table 8. S32K1xx - JTAG and SWD interface" and "Figure 11". "JTAG/SWD signal connections". Or you can send me the minimum circuit part of the schematic for me to check. Also note that the LDO powering the S32K144 needs to provide at least 250mA (see ERR052094 for details). Re: FS32K144UAT0VLLT第97脚PTA5(RESET)出现三角波电平 Robin_Shen: Hello teacher: 1. Enter the command "unlock kinetis" in J-Link, and the response will be: 11.png This means it has been successfully unlocked, right? 2. However, measuring the PTA5 reset pin still yields a triangular wave: 222.png 3. When the circuit board and the host computer download software are connected, as shown in the image below when viewing the kernel, the reset pin level should be a straight 4V line. Once the window below is closed, the reset pin changes to a triangular wave again. Is this normal? Furthermore, after the chip is unlocked, a reset signal line needs to be added when making SWDIO connections, otherwise the connection cannot be made. Why is this? Thanks! 33.png Re: FS32K144UAT0VLLT第97脚PTA5(RESET)出现三角波电平 1. Yes. Then you need to download the program to the chip so that the reset pin returns to a high level. 2. The WeChat article mentions that if there is no code in the Flash memory (e.g., in a new chip where the Flash is empty), the MCU will continuously reset periodically due to a core lockup . This explains why a triangular wave is observed on the reset pin of an empty chip when a capacitor is connected, and periodic pulses are observed when no capacitor is connected. 3. During the connection, reset, download, or programming process, the CPU is usually halted. Once halted, the CPU will not reset. However, why is the reset level only 4V? Please allow me to confirm again whether the debugging interface circuit is correct: Table 8. S32K1xx - JTAG and SWD interface AN5426.png The S32K1's reset signal needs to be connected to the debugger's reset signal.
View full article
Guider v1.8.1 的下载地址在哪里? 你好, 目前,我有一个项目需要用 GUI Guider v1.8.1 打开。但是,我在公共网站上再也找不到 GUI Guider v1.8.1 的下载链接了。 请问我可以在哪里下载这个版本? 谢谢。 图形用户界面引导器 Re: Where is the download Guider v1.8.1 嗨@IKnow 抱歉,目前我们只提供最新版本(GUI Guider v1.10.1)。下载链接。 快速创建现代化的嵌入式图形用户界面 | 恩智浦半导体 BR 哈里
View full article
I want to run Qt Application on Yocto with wayland backend.    I want to run Qt Application with wayland backend base on iMX9332 + Linux 6.12.49 and rootfs extracted from imx-image-full-imx93evk.wic.   But  an error occurred: qt.qpa.wayland: qtvirtualkeyboard currently is not supported at client-side, use QT_IM_MODULES=qtvirtualkeyboard at compositor-side.  How to use the QT qtvirtualkeyboard?  Thanks! Yocto Project Re: I want to run Qt Application on Yocto with wayland backend. Hello @OscarLi  Hope you are doing very well. The imx-image-full image uses Weston as the default Wayland compositor. Weston handles input methods through weston.ini, located at /etc/xdg/weston/weston.ini. In that file you need add the [input-method] and set QT virtual keyboard framework. Something like: [input-method] path=/usr/libexec/qtvirtualkeyboard-path Then, export: export QT_IM_MODULE=qtvirtualkeyboard ./your-qt-application -platform wayland Also, you can try: export QT_IM_MODULE=wayland ./your-qt-application -platform wayland Best regards, Salas.
View full article
22-Pin MIPI-DSI Display for FRDM i.MX 93 Hi, I am using FRDM i.MX 93 and looking for the compatible display to attach to 22-Pin MIPI-DSI port. Prefer to have the size of ~5/5.5 inch that can piggyback on the board. I found RK055HDMIPI4MA0 display, but only supports 40-pin FPC and 7inch display from Waveshare but not very sure of the model yet. Can anyone please share the information of the model that is officially supported or the experience of using the display that are not officially supported in NXP's Yocto BSP Linux here?  thank you. Re: 22-Pin MIPI-DSI Display for FRDM i.MX 93 Thank you very much @Zhiming_Liu . Will try this out. Re: 22-Pin MIPI-DSI Display for FRDM i.MX 93 Hi @KoThi  You can refer to this product link in an earlier submission. https://github.com/nxp-imx-support/meta-imx-frdm/blob/lf-6.6.36-2.1.0/meta-imx-bsp/recipes-kernel/linux/linux-imx/0004-Add-DSI-Panel-for-imx93.patch#L224 Best Regards, Zhiming
View full article
MCXA174:J-FLASHデバイスリストにMCXA174/3デバイスがなく、消去・読み取り・プログラムもできません。どうやって直せばいいですか? 現在MCXA174チップを使用しており、J-Linkでコードをプログラムする必要があります。しかし、J-Flashでプロジェクトを作成し、デバイス選択のステップに進むと、MCXA174/3チップを選択できるオプションがありません。代替デバイスとしてMCXA15XとMCXA344を選択してみましたが、どちらも動作しませんでした。どうすればいいですか?ありがとう。 SEGGER JLINK ソフトウェアバージョン V9.52 dylan_yu_0-1782201264463.png MCXA Re: MCXA174:J-FLASH device list has no MCXA174/3 DEVICE, cannot erase\read\program, how to fix it? 私が持っているのはJ-Linkという汎用バーナーだけです。他に使い道はありますか?NXPはデバイスを追加するために必要なファイル(例えば.xml)を提供できますか?.jlinkscript、そして.FLMファイル?そうでなければ、ユーザーにとってあまりにも親切ではありません。 Re: MCXA174:J-FLASH device list has no MCXA174/3 DEVICE, cannot erase\read\program, how to fix it? Hello NXPは、サードパーティ製ツールベンダーが開発環境に特定のデバイスのサポートを追加するタイミングを管理していません。ツールページの最新バージョンのリリースノート時点で、MCXA174/3はまだ掲載されていません。 MCXA174をプログラムしたい場合は、NXPのデバッガをMCUリンクとして使うことができます。 この件についてさらに情報が必要な場合はお知らせください。 よろしくお願いいたします。 Re: MCXA174:J-FLASH device list has no MCXA174/3 DEVICE, cannot erase\read\program, how to fix it? こんにちは、 このデバイスのサポートのローンチバージョンを確認するために、Seggerサポートに確認することをお勧めします。 さらに、Seggerのページからいくつかリンクを見つけたので、役立つかもしれません。 J-Linkデバイスサポートキット - SEGERナレッジベース 新しいデバイスを追加するセクションがあります NXP MCX A - SEGGERナレッジベース には、MCXAファミリの情報が含まれており、以下の情報も含まれますMCXA174 よろしくお願いいたします。
View full article
Guider v1.8.1のダウンロードはどこにありますか? こんにちは、 現在、GUI Guider v1.8.1で開く必要があるプロジェクトがあります。しかし、公開ウェブサイトでGUI Guider v1.8.1のダウンロードリンクが見つかりません。 このバージョンをダウンロードできる場所を教えていただけますか? ありがとう。 GUIガイド Re: Where is the download Guider v1.8.1 こんにちは@IKnow 申し訳ございませんが、現在提供しているのは最新バージョン(GUI Guider v1.10.1)のみです。ダウンロードリンク。 現代的な組み込みGUIファストを作成 |NXP Semiconductors BR ハリー
View full article
S32k144でバックドアアクセスキーを使った解析 プロジェクト開始前に、s32k144を使用してバックドアテストを検証したいです。 unsecureProjectに関するサンプルコードがあります。(Example_S32K144_Verify_Backdoor_Access_Key_S32DS1.3_v2.zip) サンプルコードとリファレンスマニュアルを比較して、いくつか質問があります。 1.Verify Backdoor Access Keyに関するリファレンス・マニュアルによると、以下の表のように記載されています。 LGI_0-1782174796203.png FCCOB 番号 0 はコマンド時に使用されます。 しかし、コードでは、コマンドのときにFCCOB番号4が使用されます。 LGI_1-1782174829617.png だから考えたんだ。 FTFC->FCCOB[0x0] = 0x45; // バックドアキー検証コマンド (0x45) FTFC->FCCOB[0x3] = 0x45; // バックドアキー検証コマンド (0x45) どちらが正しいですか? 2. ロックとアンロック(バックドアアクセスの確認)機構を確認したい。 初め。T32を使用してバックドアキーを設定します。(普通のやり方ではないことは分かっています。)通常はコードを挿入します) 例) Data.Set SD:0x400 %LE %Long &pwd_Head データ.Set SD:0x404 %LE %Long &pwd_Tail データ.Set SD:0x40C %LE %Long 0xFFFF7FBF 2番。リセットすると、FSECレジスタ(0x40020002)はフラッシュ構成フィールド(0x40C)のセキュリティバイトに格納された値で初期化されます。 Q.2-1。これは、デバイスがリセットされるまで非セキュア状態のままであり、リセット後にFSECレジスタ(0x40020002)が0x40Cから読み取られた値で更新され、デバイスがセキュア状態に入るという意味でしょうか? LGI_2-1782175329362.png 三番目。バックドアアクセスを確認する際、以下のリファレンス・マニュアルに「キャプチャ」と記載されています。 LGI_3-1782175422077.png Q. 2-2.これは、FSECレジスタが一時的に非セキュアモードに変更され、リセット後に元の状態に戻るという意味でしょうか?リセット時に、FSECレジスタ(0x40020002)は再び0x40Cから値を読み取る、ということですよね? 問2-3この更新が行われるとき、セキュリティ関連ビットだけが変更されるのか、それともFSECバイト全体が上書きされるのか? 例えば、遷移はBF → FEなのか、それともBF → BEなのか? 3. この説明に基づくと、キーが一致しない場合、デバイスはリセットされるまで保護されたままになります。この場合、バックドアアクセスが無効化された場合、どのようにデバイスをリセットできますか? LGI_4-1782176250749.png 4. 次のコマンドを実行すると: データ.Set AD:0x40020000 %バイト 0x30 そしてすぐに、以下の方法で読み返してください。 データ.Byte(AD:0x40020000) 値は依然として0x80のままです。 この行動の理由は何で、それは何を意味するのでしょうか? ================================================================== だから、私は思う S32K144にデータを書き込む際、設定値は0x400~0x40Fの領域に書き込まれます。 MCUがリセットまたは再起動されると、FTFCレジスタは0x400–0x40F領域に保存された設定値を読み取り、その設定に従って動作します。 右? また、バックドア比較キーがstartup_S32K144.Sに現れますが、これはmain()に入る前に設定が適用されるという意味でしょうか? ================================================= アドレス0x40000100または0x40000104を使用して、セキュリティ保護されていない状態を確認します。 これは正しいですか? リファレンス・マニュアルには関連する説明が見つかりませんでした。 ありがとう。 #s32k144 @backdoor アクセス Re: Verfiying Backdoor access key using in S32k144 サポートありがとうございます!! Re: Verfiying Backdoor access key using in S32k144 こんにちは、 @LGI さん。 A4フォローアップ: アドレス0x40020000にFSTATレジスタがあります。 前述の通り、このレジスタは0から1までのビットを設定する書き方はできません。 ビットに「1」を書き込むとクリアされるだけです(W1C – Write-1-to-clear)。したがって、「1」を書き込んでもビットは設定されず、既に「1」になっているビットがクリアされるだけです。 A8のフォローアップ: これらはMDM-APの状態および制御レジスタで、Arm Debugアクセスポート(DAP)を通じてのみアクセス可能です。 例えば、このスクリプトでは使用されています。 https://community.nxp.com/t5/S32K-Knowledge-Base/Lauterbach-Script-For-MDM-AP-Mass-erase-S32K142/ta-p/2336449 よろしくお願いいたします。 ダニエル Re: Verfiying Backdoor access key using in S32k144 ご回答ありがとうございます。@danielmartynek それでは、いくつか質問がありますので、お答えください。 A4。アドレス0x40020000に0x30を書き込みましたが、読み戻したときに値は0x30に変わらず、0x80のままでした。 この行動の理由は何で、それは何を意味するのでしょうか? Q8.これは実際にはTrace32の例に関連しています。 S32K144のTrace32例では、セキュリティ状態情報のためにアドレス0x40000100と0x40000104が使われています。 しかし、0x40000100と0x40000104の住所に関する情報は見つかりませんでした。私が質問しているのはまさにその点です。 再開まで今しばらくお待ちください。 Re: Verfiying Backdoor access key using in S32k144 こんにちは、 @LGI さん。 A1: これは FTFC->FCCOB[0x3] = 0x45; // バックドアキー検証コマンド (0x45) です。 FCCOB0はメモリマップの4番目のレジスタだからです。 danielmartynek_0-1782199747739.png A2: プログラマーやデバッガを使ってフラッシュ構成フィールドをプログラムできますが、セクターは事前に消去しておく必要があります。一括消去を行うと、FSECバイトも非セキュア状態にプログラムされることに注意してください。 A2.1: はい A2.2: はい A2.3:FSEC[SEC]のみ。 A3:MCUには多くのリセットソースがあります(RM、25.2.2システムリセットソース)。 デバッガはピン(PTA5)をアサートすることでMCU Reset_bリセットできます。 A4: レジスタへの書き込みにはW1C機能のみがあります。 danielmartynek_1-1782200487390.png Q5: S32K144にデータをプログラムする際、設定値は0x400~0x40Fの領域に書き込まれます。 A5: はい Q6: MCUがリセットまたは再起動されると、FTFCレジスタは0x400–0x40F領域に保存された設定値を読み取り、それらの設定に従って動作します。 A6: はい、MCUはフラッシュ構成フィールドの値をFTFCレジスタに読み込みます。 Q7: また、バックドア比較キーはstartup_S32K144.Sに現れますが、これはmain()に入る前に設定が適用されるという意味でしょうか? A7: リセットが必要ですが、これはプログラマー/デバッガーがプログラミング後に通常行うことです。 Q8: アドレス 0x40000100 または 0x40000104 を使用して、セキュリティ保護されていない状態を確認します。これは正しいですか? A9:私はあなたが言っているような人間ではありません。詳しく説明してください。 よろしくお願いいたします。 ダニエル
View full article
HSEファームウェアのインストール luojing_0-1782185681956.png 上記の図に示されているHSE-Bファームウェアリファレンスマニュアルのドキュメントはどこでダウンロードできますか?ダウンロードリンクを提供してください。ありがとうございます。 Re: HSE Firmware Installation こんにちは、羅京さん 既に秘密保持契約書(NDA)に署名済みの方は、文書に記載されている手順に従って登録し、NDAをアップロードしてください。https://www.nxp.com.cn/docs/en/user-guide/nxp-secure-access-rights-registration.pdf 次に、RM00286 HSE-B ファームウェア リファレンス・マニュアル - V2.7が表示されます。 download RM00286 HSE-B Firmware Reference Manual - V2.7 Secure File.png よろしくお願いいたします ロビン
View full article
适用于 FRDM i.MX 93 的 22 引脚 MIPI-DSI 显示屏 您好, 我正在使用 FRDM i.MX 93,正在寻找可连接到 22 针 MIPI-DSI 端口的兼容显示器。最好是尺寸在 5/5.5 英寸左右,可以背靠背安装在主板上的那种。我找到了 RK055HDMIPI4MA0 显示屏,但它只支持 40 针 FPC 和 Waveshare 的 7 英寸显示屏,但我还不太确定具体型号。请问有人可以分享一下NXP Yocto 电路板支持包。Linux官方支持的显示器型号信息,或者分享一下使用非官方支持的显示器的经验吗? 谢谢! Re: 22-Pin MIPI-DSI Display for FRDM i.MX 93 非常感谢@Zhiming_Liu 。我会试试。 Re: 22-Pin MIPI-DSI Display for FRDM i.MX 93 嗨@KoThi 您可以在之前提交的内容中引用此产品链接。 https://github.com/nxp-imx-support/meta-imx-frdm/blob/lf-6.6.36-2.1.0/meta-imx-bsp/recipes-kernel/linux/linux-imx/0004-Add-DSI-Panel-for-imx93.patch#L224 此致, 志明
View full article