I am currently using the MCXA174 chip and need to program code with J-Link. However, when creating a project in J-Flash and reaching the device selection step, there is no available option for the MCXA174/3 chip. I have tried selecting MCXA15X and MCXA344 as alternative devices, but none of them worked. What should I do? Thank you.
SEGGER JLINK Software version V9.52
dylan_yu_0-1782201264463.png
I only have a j-link, which is a general-purpose burner. Is there any other way to use it? Can NXP provide the necessary files to add the device, such as .xml, .jlinkscript, and .FLM files? If not, it would be too unfriendly to users.
Hello
NXP does not control for when third-party tool vendors add support for specific devices to their development environments; As of the release notes for most recent versions on the tool page, the MCXA174/3 is not listed yet.
If you want to program the MCXA174, you could use debuggers from NXP as the MCU Link.
Let me know if you need more information on this
Best Regards
Hello,
I would recommend checking with Segger support to verify a launching version for the support on this device.
Additional, I found some links from Segger page that could be helpful for you.
J-Link Device Support Kit - SEGGER Knowledge Base Has a section on adding new devices
NXP MCX A - SEGGER Knowledge Base has the MCXA family information including MCXA174
Best Regards.