2384677_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2384677_en-US

2384677_en-US

22-Pin MIPI-DSI Display for FRDM i.MX 93

Hi,

I am using FRDM i.MX 93 and looking for the compatible display to attach to 22-Pin MIPI-DSI port. Prefer to have the size of ~5/5.5 inch that can piggyback on the board. I found RK055HDMIPI4MA0 display, but only supports 40-pin FPC and 7inch display from Waveshare but not very sure of the model yet. Can anyone please share the information of the model that is officially supported or the experience of using the display that are not officially supported in NXP's Yocto BSP Linux here? 

thank you.


Re: 22-Pin MIPI-DSI Display for FRDM i.MX 93

Thank you very much @Zhiming_Liu . Will try this out.

Re: 22-Pin MIPI-DSI Display for FRDM i.MX 93

Hi @KoThi 


You can refer to this product link in an earlier submission.


https://github.com/nxp-imx-support/meta-imx-frdm/blob/lf-6.6.36-2.1.0/meta-imx-bsp/recipes-kernel/li...

Best Regards,
Zhiming

Tags (1)
No ratings
Version history
Last update:
‎06-24-2026 02:27 AM
Updated by: