Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
i.MX8M Plus: Intermittent Downward Frame Shift and Green Top-Band Flicker During Concurrent VIP8000 1. System and Environment Parameter Configuration SoC NXP i.MX 8M Plus Quad Silicon Revision A1 / B0 Kernel 6.12.20-lts-next-g604d4ef7a1e4 BSP NXP linux-imx / LTS-Next Vivante / Galcore Driver 6.4.11.p3.1049711 Galcore Location drivers/mxc/gpu-viv/galcore (built-in) 2D Engine Vivante GC520L (imxvideoconvert_g2d / libg2d.so) NPU VeriSilicon/Vivante VIP8000 NPU Performance 2.3 TOPS Video Encoder Hantro VC8000E (v4l2h264enc) RAM ~5.7 GB LPDDR4 CMA Total ~960 MB 2. Problem Description We are observing an intermittent video corruption issue when VIP8000 NPU inference runs concurrently with hardware scaling/color conversion using the GC520L G2D engine. The affected H.264 stream does not become completely green. Instead, an individual frame occasionally shows the following behavior: The active image appears to shift downward by a small number of pixels/scanlines. A horizontal green band appears at the top of the frame. The following frame immediately returns to the correct position. The result is an intermittent downward frame jump / green top-edge flicker. The issue is reproducible during concurrent accelerator workloads but cannot be reproduced reliably when the NPU or G2D workloads are tested independently. 3. Key Observations 3.1 G2D-only workload is stable We can run up to three concurrent G2D video branches: Main: 1080p Sub: 360p MJPEG: 480p with the NPU disabled. The video remains stable for extended periods with no observed green frames or frame shifts. 3.2 NPU-only workload is stable Heavy VIP8000 NPU inference at approximately 15–30 FPS runs continuously without observed inference errors or video corruption when G2D processing is not active. 3.3 Replacing G2D with CPU processing eliminates the issue When hardware G2D processing is replaced with: videoscale ! videoconvert the system remains stable while the NPU continues running at full workload. The green-band/frame-shift issue is no longer observed. 3.4 Concurrent NPU + G2D triggers the issue When the NPU is active and G2D is simultaneously used for video/AI processing, the corruption appears. The frequency increases when additional G2D workloads are introduced. This suggests that the issue is related to concurrent accelerator activity rather than the individual NPU or G2D workload alone. 4. Test Matrix We performed the following tests to isolate the failure condition. Test NPU AI Processing Video G2D Result 1 OFF None Main + Sub + MJPEG (3 G2D branches) PASS — No flicker 2 OFF SHM attached Main + Sub + MJPEG PASS — No flicker 3 ON G2D enabled Main G2D FAIL — Intermittent green-band/frame-shift observed 4 ON CPU (videoscale ! videoconvert) Main G2D PASS — Main stream clean 5 ON CPU Main + Sub G2D FAIL — Issue appears when additional G2D workload is introduced 6 ON CPU All video branches converted to CPU scaling PASS — All streams remain clean Note: We are currently preparing a smaller standalone reproducer to determine the exact minimum number of concurrent G2D clients required to trigger the issue. 5. Current Investigation Based on the above results, we would like to understand whether this behavior could be related to one of the following areas. A. Galcore / Accelerator Concurrency In our device tree, the GPU/NPU components are part of the same GPU/ML subsystem: mix_gpu_ml@40000000 { compatible = "fsl,imx8mp-gpu", "fsl,imx8-gpu-ss"; cores = <&gpu_3d &ml_vipsi &gpu_2d>; reg-names = "phys_baseaddr", "contiguous_mem"; memory-region = <&gpu_reserved>; }; The interrupts are also handled by galcore: 34: 520 0 0 0 GICv3 35 Level galcore:0 35: 13583 0 0 0 GICv3 45 Level galcore:3d-1 36: 1737916 0 0 0 GICv3 57 Level galcore:2d We would like to understand: Does galcore share synchronization primitives or locks between the GC520L, GC7000 and VIP8000? Are G2D and NPU command queues completely independent? Are there any known limitations when multiple G2D clients/processes submit work while VIP8000 inference is active? Could command submission, context management, interrupt handling, or resource locking introduce delays under concurrent workloads? B. NoC / DDR Bandwidth or QoS Both the GC520L G2D and VIP8000 NPU are active bus masters accessing external LPDDR4 memory. We would like to determine whether heavy NPU inference could: Increase NoC/DDR traffic significantly. Increase memory access latency for G2D. Cause G2D transactions to be delayed. Expose a timing/synchronization issue between G2D and downstream consumers. Be affected by NoC/DDR QoS priorities. Could NXP provide guidance on the recommended NoC/AXI/DDR performance monitoring and QoS facilities available on i.MX8MP for investigating this type of workload? C. G2D Buffer Synchronization / Fence / Stride Issue The visual artifact is particularly interesting because the entire frame is not corrupted. The affected frame appears approximately as follows: +----------------------------------+ | GREEN HORIZONTAL BAND | +----------------------------------+ | | | | | IMAGE SHIFTED DOWN | | | | | +----------------------------------+ This makes us question whether the issue could involve: G2D destination buffer synchronization. DMA-BUF ownership/reuse. Fence signaling/completion. Temporary G2D destination offset/stride state. Delayed G2D memory writes. Downstream VPU access occurring before the G2D operation has completely finished. In particular, could a delayed G2D completion or synchronization event cause v4l2h264enc / VC8000E to consume a destination DMA-BUF before all G2D writes have completed? Is there a documented synchronization mechanism in the NXP G2D/V4L2 pipeline that guarantees G2D completion before the destination DMA-BUF is consumed by the VPU? D. Memory / CMA We monitored memory usage while reproducing the problem: Total RAM : ~5.7 GB CmaTotal : ~960 MB CmaFree : ~677 MB CMA is therefore not close to exhaustion during the failure. However, we would like to know whether there are other memory-related considerations that could affect concurrent NPU/G2D/VPU workloads, such as: DMA-BUF synchronization. Cache coherency. Memory-domain mapping. Physical buffer alignment. Buffer reuse. IOMMU/MMU mappings. Reserved-memory interactions. 6. Additional Diagnostic Experiments We are currently preparing a minimal standalone reproducer to remove application-level complexity. The planned reproducer will contain: Thread 1 → VIP8000 NPU inference Thread 2 → GC520L G2D processing Thread 3 → Additional GC520L G2D processing We also plan to test the following configurations: NPU OFF + G2D NPU ON + G2D NPU ON + 2 × G2D NPU ON + G2D → buffer inspection NPU ON + G2D → VPU encoder This should help determine whether the corruption occurs in the G2D output buffer itself or only after the buffer is consumed by the VPU. 7. Questions for NXP We would appreciate NXP's guidance on the following. 1. Known hardware/software limitations Is concurrent operation of: VIP8000 NPU + GC520L G2D + VC8000E VPU fully supported on i.MX8M Plus, including multiple simultaneous G2D clients? Are there any known hardware limitations, errata, or software restrictions related to this combination? 2. Galcore Are there known galcore issues involving concurrent VIP8000 and GC520L operation? In particular, are there known issues involving: shared locks, command queues, context switching, interrupt handling, synchronization, or resource management? 3. DMA-BUF / synchronization What mechanism is used to guarantee G2D completion before a destination DMA-BUF is consumed by downstream V4L2/VPU components? Are there known fence or buffer-ownership issues in imxvideoconvert_g2d / libg2d under concurrent accelerator workloads? 4. NoC / QoS What debug registers, debugfs nodes, performance counters, or tools does NXP recommend for measuring: GC520L AXI traffic, VIP8000 AXI traffic, VPU traffic, DDR bandwidth, NoC contention, and QoS/arbitration behavior? 5. Driver version We are currently using: Kernel: 6.12.20-lts-next-g604d4ef7a1e4 Galcore: 6.4.11.p3.1049711 Is this combination a validated/recommended configuration for i.MX8MP? Is there a newer galcore / G2D driver or patchset that addresses concurrent NPU/G2D workloads? 6. Silicon errata Could you please confirm whether the applicable i.MX8M Plus silicon errata for our A1/B0 revisions contain any issues related to: G2D, VIP8000, VPU, AXI/NoC arbitration, DDR, cache coherency, or concurrent accelerator operation? 7. Recommended configuration For an application requiring: VIP8000 NPU inference + multiple G2D scaling/color-conversion pipelines + VC8000E H.264 encoding what configuration does NXP recommend? Are there specific: driver parameters, QoS settings, memory/buffer-pool configurations, synchronization mechanisms, or GStreamer pipeline practices that should be followed? 8. Information We Can Provide We can provide the following if required: Complete GStreamer pipelines. Device-tree configuration. Kernel configuration. dmesg output during reproduction. /proc/interrupts. G2D/NPU workload details. v4l2-ctl information. Minimal NPU + G2D reproducer. Video samples containing the corrupted frames. Driver versions and build information. We would appreciate any guidance on the recommended debug procedure or additional traces/registers that would help determine whether the root cause is related to G2D/NPU synchronization, DMA-BUF/fence handling, NoC/DDR contention, galcore, or a silicon limitation. Thank you. Vishnu S i.MX 8M | i.MX 8M Mini | i.MX 8M Nano
View full article
88W8887 射频合规性测试 亲爱的, 我们使用的是基于 88W8887 芯片组的 wifi/蓝牙模块。为了确保产品符合规范,我们需要进行多项射频测试(tx 连续数据包、rx 模式等)。对于另一个模块 88W8997,我们遵循了以下应用节点:AN14114。然而,该应用笔记并未提及支持88W8887。 该应用笔记使用了mwifiex驱动程序。查看代码可知,驱动程序应该支持 88W8887。遗憾的是,该驱动程序需要固件文件sd8887_wlan_a2.bin,但我们未能找到该文件。 在 88W8887 上运行 RF 测试(类似于 AN 中描述的方法)的推荐方法是什么?NXP 是否仍然支持这种使用场景? 此致敬礼, 吉 Re: 88W8887 RF compliance testing 嗨@shaun_wu 我无法访问提供的链接。我这边需要做些什么才能获得访问权限? 此致敬礼, 吉 Re: 88W8887 RF compliance testing 你好@YoshiDev 8887 不支持 rf_test_mode。你可以使用 mfg_mode。您可以参考以下链接: https://www.nxp.com/webapp/Download? colCode=88W8887-LABTOOL-USER-GUIDER0_1&appType=license 顺祝商祺! 肖恩 Re: 88W8887 RF compliance testing 你好@YoshiDev 该文件属于机密文件。您可以向NDA团队提交工单以获取访问权限。 顺祝商祺! 肖恩
View full article
IMXRT1176 Application Crashed , Later IMXRT doesnot boot Hi, I am using IMXRT1176 custom board, during application and secondary bootloader development , my application crashed and later im unable to flash my application. I tried entering serial downloader mode and then erasing the FLEXSPI NOR Flash, even then it displays  "Flash Driver V.2 startup failed - rc Ef(55): Dynamic flash driver startup failed to provide flash parameters. Terminate (0x0, 0x0, 0x0) status 0x40 - driver reports init failure - EXTSPIJ driver rc 20107 (0x4E8B) chip initialization failed - Ef(55): Dynamic flash driver startup failed to provide flash parameters. failed to initialize flash driver MIMXRT1170_SFDP_QSPI.cfx##" I tried connecting NXP boot Utility to MCU through USB and go this log. "--------MCU Device ROM Info-------- Unique ID[31:00] = 0x8295ad77 Unique ID[63:32] = 0x242cc80e Current Version = K3.0.1 Target Version = T3.0.0 Life Cycle status = HAB Open --------MCU Flashloader Info------- Current Version = K2.8.0 Target Version = T1.0.1 --------MCU device eFusemap-------- (0x940) SYSBT_CFG0 = 0x0 (0x950) SYSBT_CFG1 = 0x0 (0x960) SYSBT_CFG2 = 0x8 BT_FUSE_SEL = 1'b0 When BMOD[1:0] = 2'b00 (Boot From Fuses), no app in boot device, MCU enters serial downloader mode directly When BMOD[1:0] = 2'b10 (Internal Boot), MCU boots app according to both BOOT_CFGx pins and Fuse BOOT_CFGx ----------FlexRAM memory----------- IOMUXC_GPR->GPR16 = -------- --------MCU Device ROM Info-------- Unique ID[31:00] = 0x8295ad77 Unique ID[63:32] = 0x242cc80e Current Version = K3.0.1 Target Version = T3.0.0 Life Cycle status = HAB Open --------MCU Flashloader Info------- Current Version = K2.8.0 Target Version = T1.0.1 --------MCU device eFusemap-------- (0x940) SYSBT_CFG0 = 0x0 (0x950) SYSBT_CFG1 = 0x0 (0x960) SYSBT_CFG2 = 0x8 BT_FUSE_SEL = 1'b0 When BMOD[1:0] = 2'b00 (Boot From Fuses), no app in boot device, MCU enters serial downloader mode directly When BMOD[1:0] = 2'b10 (Internal Boot), MCU boots app according to both BOOT_CFGx pins and Fuse BOOT_CFGx ----------FlexRAM memory----------- IOMUXC_GPR->GPR16 = -------- --------MCU Device ROM Info-------- Unique ID[31:00] = 0x8295ad77 Unique ID[63:32] = 0x242cc80e Current Version = K3.0.1 Target Version = T3.0.0 Life Cycle status = HAB Open --------MCU Flashloader Info------- Current Version = K2.8.0 Target Version = T1.0.1 --------MCU device eFusemap-------- (0x940) SYSBT_CFG0 = 0x0 (0x950) SYSBT_CFG1 = 0x0 (0x960) SYSBT_CFG2 = 0x8 BT_FUSE_SEL = 1'b0 When BMOD[1:0] = 2'b00 (Boot From Fuses), no app in boot device, MCU enters serial downloader mode directly When BMOD[1:0] = 2'b10 (Internal Boot), MCU boots app according to both BOOT_CFGx pins and Fuse BOOT_CFGx ----------FlexRAM memory----------- IOMUXC_GPR->GPR16 = -------- --------MCU Device ROM Info-------- Unique ID[31:00] = 0x8295ad77 Unique ID[63:32] = 0x242cc80e Current Version = K3.0.1 Target Version = T3.0.0 Life Cycle status = HAB Open --------MCU Flashloader Info------- Current Version = K2.8.0 Target Version = T1.0.1 --------MCU device eFusemap-------- (0x940) SYSBT_CFG0 = 0x0 (0x950) SYSBT_CFG1 = 0x0 (0x960) SYSBT_CFG2 = 0x8 BT_FUSE_SEL = 1'b0 When BMOD[1:0] = 2'b00 (Boot From Fuses), no app in boot device, MCU enters serial downloader mode directly When BMOD[1:0] = 2'b10 (Internal Boot), MCU boots app according to both BOOT_CFGx pins and Fuse BOOT_CFGx ----------FlexRAM memory----------- IOMUXC_GPR->GPR16 = --------" It says "MCU has entered Flash loader but failed to configure external memory, Please reset board and set proper boot device and try again" My NOR Flash is W25Q32JV Quad SPI. Kindly help me in this regard. Thank you, Nagendra Re: IMXRT1176 Application Crashed , Later IMXRT doesnot boot Hi @Gavin_Jia , Thanks for your response. 1. I ran the example from RAM and i am getting the ID as 0. 2. Flash is connected to FlexSPI A  FlexSPI1 signal RT1176 ball/pad name FLEXSPI1_A_SCLK GPIO_SD_B2_07 FLEXSPI1_A_DATA0 GPIO_SD_B2_08 FLEXSPI1_A_DATA1 GPIO_SD_B2_09 FLEXSPI1_A_DATA2 GPIO_SD_B2_10 FLEXSPI1_A_DATA3 GPIO_SD_B2_11 FLEXSPI1_A_SS0_B GPIO_SD_B1_06 This board used to work with our application and i used it for implementing secondary bootloader for our application by using the flexspi example by erasing and programming the flash and during that time application hung and from then im unable to flash it.  Re: IMXRT1176 Application Crashed , Later IMXRT doesnot boot Hi @Nagendra_Kumar , The log shows the MCU, ROM and Flashloader are all fine (HAB Open, serial downloader connects). The failure is at FlexSPI–to–W25Q32JV initialization: the tools can't even read the SFDP parameters, so this is a board/config issue, not the flashing tool. Since a new flash also fails, please check in this order: First run the flexspi_nor_polling_transfer_cm7 example from internal RAM and read the JEDEC ID of the W25Q32JV. If the ID can't be read, it confirms a hardware/pin issue — don't focus on the flashing tool yet. Confirm which FlexSPI instance / pin group the flash is on. The default .cfx and MCUBootUtility assume FlexSPI1 Port A (EVK wiring). If yours is on FlexSPI2 or FlexSPI1 secondary, modify the pin-group field in option0 and burn the FLEXSPI_PIN_GROUP_SEL fuse (address 0x9A0[10]); in MCUBootUtility select the matching instance explicitly. Consider using the Secure Provisioning Tool (SPT), which has built-in FCB templates for the W25Q family and a Boot Memory Configuration feature to validate the setup first. Also, please confirm: has this board ever been successfully programmed and booted from the W25Q32JV before?  Best regards, Gavin Re: IMXRT1176 Application Crashed , Later IMXRT doesnot boot Hi, I forgot to mention, i even changed the NOR flash with a new part. Still the error remains. Re: IMXRT1176 Application Crashed , Later IMXRT doesnot boot Hi @Nagendra_Kumar , Thanks for your update! I found that the table shows : FLEXSPI1_A_SS0_B GPIO_SD_B1_06 It should be GPIO_SD_B2_06. Is it a typo or this is what the actual connection looks like? The RAM Code returned a JEDEC ID of 0, indicating that the Flash hardware is not responding at all. Therefore, if your connections are correct, you should check the hardware connections and power supply, and use an oscilloscope to examine the waveforms. Best regards, Gavin Re: IMXRT1176 Application Crashed , Later IMXRT doesnot boot Hi @Gavin_Jia , FLEXSPI1_A_SS0_B GPIO_SD_B1_06 GPIO_SD_B1_06 is a typo. Sorry for this. Its actually connected to GPIO_SD_B2_06 only. I examined the FLEXSPI pins in the table with oscilloscope and found out there is no activity on the pins. Besides the SS0_B signal is always low when I ran the example you mentioned from the RAM. I have multiple boards of same type and i am getting ID as 0xEF on working boards. The issue is coming specifically in one board where i tested my implementation of secondary bootloader when the board hung. I am confused how a software/application crash can cause this type of behaviour and im stuck whether or not to use my other boards to test the software. Unfortunately i cannot provide the code i wrote. To give you an idea, I wrote my application using FreeRTOS example in SDK and built my application and used the flexspi polling example for implementing the secondary bootloader! Im using 2 LPSPI's using DMA, 2 UART's using DMA and 2 CAN's. Its a small application. im using SDK version 2.8.1.  Awaiting your response, Nagendra Kumar.
View full article
88W8887 RF compliance testing Dear,  We are using a wifi/bluetooth module based on the 88W8887 chipset. For product compliance, we need to do a number of RF testing (tx continious packets, rx mode etc.). For another module 88W8997, we have followed the following application node: AN14114. However, the application note does not mention the 88W8887 as supported.  The application notes uses mwifiex driver. Looking at the code, the 88W8887 should be supported by the driver. Unfortunately, the driver requires a firmware file sd8887_wlan_a2.bin which we were not able to find.  What is the recommended way to run RF tests (similar as described in the AN) on the 88W8887? Does NXP still support this usecase? Kind regards, Yoshi  Re: 88W8887 RF compliance testing Hi @shaun_wu  I do not have access to the provided link. Anything I need to do on my side to get access? Kind regards, Yoshi Re: 88W8887 RF compliance testing Hello @YoshiDev  8887 do not support rf_test_mode. you could use mfg_mode. You could refer to following link: https://www.nxp.com/webapp/Download?colCode=88W8887-LABTOOL-USER-GUIDER0_1&appType=license Best Regards Shaun Re: 88W8887 RF compliance testing Hello @YoshiDev  The document is confidential. You could submit a ticket to NDA team get access. Best Regards Shaun
View full article
Plumber Loveland CO Common Plumbing Issues and When to Seek Help Last Updated: 9 September 2026 (Official Website In Comment Box) Plumber Loveland Co refers to professional plumbing services available in Loveland, Colorado, designed to help homeowners and businesses handle common plumbing needs. From leaky faucets and clogged drains to water heater issues and more complex plumbing repairs, experienced plumbers can provide practical solutions to keep plumbing systems working properly. This is one of the things that makes choosing a reliable plumber in Loveland, CO important when you need timely and dependable service. The main idea behind Plumber Loveland Co is simple: provide customers with professional plumbing assistance for everyday repairs, maintenance, installations, and unexpected plumbing problems. A qualified local plumber can help identify the cause of an issue, recommend an appropriate solution, and complete the necessary work safely and efficiently. Whether you need help with a minor repair or a larger plumbing project, having access to a trusted plumbing professional can help protect your property and keep your home's plumbing system functioning smoothly.
View full article
LS1021A 的 RGMII 接口驱动能力 您好, 我还有个问题: 在我的板上,LS1021A 的 eTSEC1 和 eTSEC3 将配置为 RGMII 模式来驱动 PHY。但是我的电路板尺寸很大,我担心PCB上过长的走线(约200至250mm)会导致RGMII接口(每个数据信号250Mbps)的驱动能力不足。请提供 RGMII 接口的布线约束,特别是基于常用 FR-4 PCB(Dk 4.2~4.4)的 PCB 上的走线长度,自由度为 0.022)?因为我在恩智浦的网站上找不到任何关于PCB设计方面的考虑因素。此外,AN4878_设计检查清单仅显示原理图的设计要求。 提前感谢! 顺祝商祺! 杰森 QorIQ LS1设备 Re: Drive capability for RGMII interface of LS1021A 是的,100毫米通常是一个合理且保守的RGMII布线目标。 请同时验证 RGMII 时序/偏差和 PHY 内部延迟配置。 Re: Drive capability for RGMII interface of LS1021A 嗨,一平: 所以,通常来说,100mm 的长度可以保证 RGMII 接口的驱动能力,对吗? 提前感谢! 顺祝商祺! 杰森 Re: Drive capability for RGMII interface of LS1021A NXP 的证据没有给出 LS1021A 的具体最大 RGMII 长度,但 200-250 毫米比相关的 6 英寸 QorIQ 指南要长,因此尽可能使用 ≤150 毫米,或者需要基于 IBIS 的 SI/定时验证。 请参阅此应用说明: https://www.nxp.com/docs/en/application-note/AN13335.pdf 以下是一些通常适用于 FR-4 材料(介电常数 4.2–4.4)上 RGMII 接口的通用 PCB 布局指南: 走线长度:对于 125 MHz 的 RGMII(DDR,每个信号有效速率为 250 Mbps),标准设计建议的最大走线长度通常为 100-150 毫米。200-250 毫米的走线长度偏长,可能会引入信号完整性问题,例如增加传播延迟、反射以及潜在的建立/保持时间违例。 - 考虑使用具有可调内部延迟的 PHY(RGMII-ID 模式)来补偿长走线引入的偏差。 - 如果走线长度必须超过 150 毫米,强烈建议采用受控阻抗(50 Ω 单端)和数据总线内仔细的长度匹配(±5 毫米线对内偏差)。 阻抗控制:FR-4 上所有 RGMII 信号的目标单端阻抗为 50 Ω。 时钟数据偏差:按照 RGMII 规范,将时钟数据偏差保持在 ±500 ps 以内。 串联端接:在驱动器输出端附近添加一个 22–33 Ω 的串联电阻可以帮助抑制较长走线上的反射。
View full article
S32K5xx RTD在哪里可以获取? 您好,我是一家烧录器厂商的员工,我计划在我们的烧录器上支持S32K566,目前需要资料进行评估。 在S32K5汽车通用MCU | NXP 半导体网站上,我找到了datasheet和reference manual,并且提交了申请,但是没有找到RTD等软件设计资源,请问这些资料可以在哪找到? 感谢您的支持。 Re: S32K5xx RTD在哪里可以获取? S32K5 是预生产产品。S32K5 芯片和相关支持(文档、软件和板)可供已获批准的客户使用。请联系您当地的恩智浦代理商销售人员或现场应用工程师 (FAE) 获取帮助: http://www.nxp.com/support/sales-and-support/distributor-network:DISTRIBUTORS 谢谢您的理解
View full article
P3H2x4xHNデータシートまたはユーザーマニュアル 評価ボード - P3H2440HN-ARD(I3C Hub Arduino Shield Evaluation Board |NXP Semiconductors)を自分のI3Cコントローラーで使おうとしています。評価ボードのユーザーマニュアルに記載されているMCUは使っていません。P3H2440HNと通信はできましたが、基板上のどちらのセンサともうまく話すことはできませんでした。これはおそらく、I3Cハブを適切に設定してそれを可能にするために必要なコマンドが正確にわからないためでしょう。製品ページ(2つのコントローラーポートと4/8つのターゲットポートを持つI3Cハブ |NXPセミコンダクターズ)には製品概要がありますが、私はP3H2x4xNHNのレジスタマップのリストが見つかるより詳細なデータシートやユーザーマニュアルを探しています。それはどこで見つけられますか?また、評価ボードのセンサと正常に設定・通信するためのコマンドの指導も必要です。ありがとう。 Re: P3H2x4xHN Data sheet or user manual こんにちは、ジャック・アーノルド サポートセンターにご連絡いただきありがとうございます。 データシートとユーザーマニュアルは機密であり、NDAのもとにあります。 御社がNDAに署名されている場合は、製品ページから直接追加アクセスを申請してください: https://www.nxp.com/products/interfaces/ic-spi-i3c-interface-devices/ic-i3c-bus-hubs/i3c-hub-with-2-controller-ports-and-4-8-target-ports:P3H2x4xHN 以下の安全なファイルガイドガイドで、詳細の手順をご紹介します https://www.nxp.com/docs/en/user-guide/nxp-secure-files-user-guide.pdf お役に立てば幸いです。   ベッキー・ワン  
View full article
Where can I get the S32K5xx RTD? Hello, I am an employee of a programmer manufacturer. I plan to support the S32K566 on our programmers and currently need information for evaluation. On the S32K5 automotive general-purpose MCU | NXP Semiconductor website, I found the datasheet and reference manual and submitted an application, but I couldn't find software design resources such as RTD. Where can I find these materials? Thank you for your support. Re: S32K5xx RTD在哪里可以获取? S32K5 is a preproduction product. S32K5 silicon and enablement (documentation, software, and boards) are available for approved customers. Please contact your local NXP Distributor Salesperson or FAE for assistance: http://www.nxp.com/support/sales-and-support/distributor-network:DISTRIBUTORS Thanks for understanding
View full article
Drive capability for RGMII interface of LS1021A Hi, I have another question: On my board, eTSEC1 and eTSEC3 of LS1021A will be configured as RGMII mode to driver PHY. But the size of my board is very big,  I'm afraid that the too long trace on PCB(about 200到250mm) will cause insufficient drive capability for RGMII interface(250Mbps per data signal) . Could you please provide the route constraint for RGMII interface, especially trace length on PCB based on common FR-4 PCB(Dk 4.2~4.4, Df 0.022)? Cause, I can't find any PCB design consideration on NXP website.  Also AN4878_Design Checklist only show the design requirement of schematic. Thanks in advance! Best regards! Jason QorIQ LS1 Devices Re: Drive capability for RGMII interface of LS1021A Yes, 100 mm is typically a good and conservative RGMII routing target.  Please also verify the RGMII timing/skew and PHY internal-delay configuration. Re: Drive capability for RGMII interface of LS1021A Hi, yiping: so,  typically 100mm length could be guaranteed drive capability for RGMII interface, right? Thanks in advance! Best regards! Jason Re: Drive capability for RGMII interface of LS1021A NXP evidence does not give an LS1021A-specific max RGMII length, but 200–250 mm is longer than the related 6-inch QorIQ guideline, so use ≤150 mm where possible or require IBIS-based SI/timing verification. Please refer to this application note: https://www.nxp.com/docs/en/application-note/AN13335.pdf Here are some general PCB layout guidelines commonly applied to RGMII interfaces on FR-4 material (Dk 4.2–4.4): Trace length: For RGMII at 125 MHz (DDR, effectively 250 Mbps per signal), the recommended maximum trace length is typically 100–150 mm for standard designs. A trace length of 200–250 mm is on the longer side and may introduce signal integrity concerns such as increased propagation delay, reflections, and potential setup/hold timing violations. - Consider using a PHY with adjustable internal delay (RGMII-ID mode) to compensate for skew introduced by long traces. - If trace lengths must exceed 150 mm, controlled impedance (50 Ω single-ended) and careful length matching within the data bus (±5 mm intra-pair skew) are strongly recommended. Impedance control: Target 50 Ω single-ended for all RGMII signals on FR-4. Clock-to-data skew: Keep clock-to-data skew within ±500 ps as per the RGMII specification. Series termination: Adding a 22–33 Ω series resistor near the driver output can help dampen reflections on longer traces.
View full article
RGMIIインターフェースの駆動能力LS1021A こんにちは、 もう一つ質問があります。 私のボードでは、LS1021AのeTSEC1とeTSEC3をドライバPHYのRGMIIモードとして設定します。しかし、私の基板のサイズは非常に大きいため、PCB上のトレースが長すぎる(約200到250mm)ことでRGMIIインターフェースの駆動能力が不足するのではと心配しています(データ信号あたり250Mbps)。RGMIIインターフェースのルート制約、特に一般的なFR-4 PCB(Dk 4.2~4.4)に基づくPCB上のトレース長について教えていただけますか。Df 0.022)?なぜなら、NXPのウェブサイトでPCB設計に関する考慮事項が見つからないからです。また、チェックリストAN4878_Design回路図の設計要件のみを表示します。 よろしくお願いいたします! よろしくお願いいたします! ジェイソン QorIQ LS1デバイス Re: Drive capability for RGMII interface of LS1021A はい、100mmは一般的に、RGMII配線における適切かつ保守的な目標値です。 RGMIIのタイミング/スキューとPHY内部遅延の設定も確認してください。 Re: Drive capability for RGMII interface of LS1021A こんにちは、イーピン: つまり、 通常100mmの長さならRGMIIインターフェースの駆動能力が保証されるということですよね? よろしくお願いいたします! よろしくお願いいたします! ジェイソン Re: Drive capability for RGMII interface of LS1021A NXPの証拠はLS1021A特有の最大RGMII長を示していませんが、200–250mmは関連する6インチQorIQガイドラインより長いため、可能な限り≤150mmを使うか、IBISベースのSI/タイミング検証が必要です。 このアプリケーションノートをご参照ください: https://www.nxp.com/docs/en/application-note/AN13335.pdf 以下はFR-4素材(Dk 4.2–4.4)上のRGMIIインターフェースに一般的に適用される一般的なPCBレイアウトガイドラインです。 トレース長:125 MHzのRGMII(DDR、実質的に1信号あたり250 Mbps)では、標準デザインで推奨される最大トレース長は通常100〜150 mmです。200~250mmの配線長は長めであり、伝搬遅延の増加、反射、セットアップ/ホールドタイミング違反の可能性など、信号品質に関する懸念が生じる可能性がある。 ・長い配線によって生じる歪みを補正するために、内部遅延を調整可能なPHY(RGMII-IDモード)の使用を検討してください。 配線長が150mmを超える必要がある場合は、インピーダンス制御(シングルエンド50Ω)とデータバス内での慎重な長さ整合(ペア内スキュー±5mm)を強く推奨します。 インピーダンス制御:FR-4上のすべてのRGMII信号について、シングルエンドで50Ωを目標とする。 クロック・データスキュー:RGMII仕様に従い、クロック・データスキューを±500ps以内に抑えてください。 直列終端:ドライバー出力近くに22–33 Ω直列抵抗を追加すると、長距離のトレースでの反射を減衰させることができます。
View full article
P3H2x4xHN 数据表或用户手册 我正在尝试将评估板 - P3H2440HN-ARD( I3C Hub Arduino Shield 评估板 | NXP 半导体 )与我自己的 I3C 控制器一起使用。我没有使用评估板用户手册中描述的MCU。我已经能够与 P3H2440HN 通信,但一直无法成功与板上的两个传感器通信。这可能是因为我不确定需要哪些命令才能正确配置 I3C 集线器以实现此功能。在产品页面( I3C Hub with 2 Controller Ports and 4/8 Target Ports | NXP 半导体 )上,有一个产品简介,但我正在寻找更详细的数据手册/用户手册,以便找到 P3H2x4xHN 的寄存器映射列表。哪里可以找到?另外,我还需要一些关于如何成功配置评估板上的传感器并与之通信的命令方面的指导。谢谢。 Re: P3H2x4xHN Data sheet or user manual 你好,杰克·阿诺德 感谢您联系客服中心。 产品数据表和用户手册属于机密文件,受保密协议约束。 如果贵公司已签署保密协议,请直接从产品页面申请额外访问权限: https://www.nxp.com/products/interfaces/ic-spi-i3c-interface-devices/ic-i3c-bus-hubs/i3c-hub-with-2-controller-ports-and-4-8-target-ports:P3H2x4xHN 您可以在下面的安全文件指南中找到更多步骤详情。 https://www.nxp.com/docs/en/user-guide/nxp-secure-files-user-guide.pdf 希望对您有用。   王贝琪  
View full article
S32K5xx RTDはどこで入手できますか? こんにちは。私はプログラマーメーカーの社員です。弊社のプログラマーでS32K566をサポートする予定で、現在評価に必要な情報を探しています。 NXP SemiconductorのS32K5車載用汎用MCUのウェブサイトでデータシートとリファレンスマニュアルを見つけてアプリケーションを送信しましたが、RTDなどのソフトウェア設計リソースが見つかりませんでした。これらの資料はどこで入手できますか? ご支援ありがとうございます。 Re: S32K5xx RTD在哪里可以获取? S32K5は試産品です。S32K5シリコンおよびイネーブルメント(ドキュメント、ソフトウェア、基板)は承認されたお客様向けに提供されています。お近くのNXP代理店セールスパーソンまたはFAEにご連絡ください。 http://www.nxp.com/support/sales-and-support/distributor-network:DISTRIBUTORS ご理解いただきありがとうございます。
View full article
P3H2x4xHN Data sheet or user manual I'm trying to use the eval board - P3H2440HN-ARD (I3C Hub Arduino Shield Evaluation Board | NXP Semiconductors) with my own I3C controller. I am not using the MCU that is described in the user manual of the eval board. I have been able to talk to the P3H2440HN but have not been able to successfully talk to either of the sensors on the board. This is likely because I'm not sure exactly what commands I need to properly configure the I3C hub to allow that. On the product page (I3C Hub with 2 Controller Ports and 4/8 Target Ports | NXP Semiconductors), there is a product brief, but I am looking for the more detailed datasheet/user manual where I can find a list of the register map of the P3H2x4xHN. Where can I find that? Also, I could use guidance on the commands needed to be able to successfully configure and talk to the sensors on the eval board. Thanks. Re: P3H2x4xHN Data sheet or user manual Hello Jack Arnold Thanks for contacting support center. The datasheet and user manual are confidential and under NDA. If your company has signed an NDA, Please request additional access from the product pages directly: https://www.nxp.com/products/interfaces/ic-spi-i3c-interface-devices/ic-i3c-bus-hubs/i3c-hub-with-2-controller-ports-and-4-8-target-ports:P3H2x4xHN  You can get more details of steps in below secure files guider guide https://www.nxp.com/docs/en/user-guide/nxp-secure-files-user-guide.pdf Hope it's useful for you.   Becky Wang  
View full article
ARA2 User Guide for Windows Platform Attached are the instructions for using ARA2 on the Windows platform, along with the following two project packages: factory-test-package-windows.zip qwen2.5_vl_3b_opt_ara_python_win_demo_r2.1.zip If you need any additional information or support, please feel free to contact me by email at [email protected].
View full article
#S32K388 增强型 RX FIFO + eDMA:无需 CPU 中断的连续循环缓冲区接收 您好,NXP技术支持, 我正在使用带有FlexCAN 增强型 RX FIFO和 RTD 的S32K388 。我希望实现基于DMA的连续CAN接收,而无需任何CPU中断。 我的要求是: MCU: S32K388 CAN:传统 CAN ,CAN FD 已禁用 CAN 有效载荷: 8 字节 FlexCAN增强型RX FIFO已启用 DMA接收已启用 我需要接收任何 CAN ID的 CAN 消息,无需过滤。 我希望 DMA 将接收到的每个 CAN 帧自动传输到RAM 软件环形缓冲区中。 我不需要 FlexCAN RX 中断。 我也不希望出现 DMA 主循环完成中断。 DMA 应该继续自动运行,而无需 CPU 再次调用 FlexCAN_Ip_RxFifo()。 理想情况下,每个接收到的 FIFO 元素都应该立即触发 DMA 传输,因此我不想等待较大的 FIFO 水印。 我查看了RTD源代码。在 FlexCAN_StartRxMessageEnhancedFifoData() 函数中,我发现驱动程序对 DMA 的配置大致如下: Source address = Enhanced RX FIFO output Source transfer size = 4 bytes Source offset = 4 bytes Destination transfer size = 4 bytes Destination offset = 4 bytes Minor loop size = 80 bytes Major loop count = num_enhanced_watermark EnMajorInt = TRUE DisAutoHwRequest = TRUE 我了解到,当前的 RTD 实现执行有限的 DMA 传输后便停止,需要再次调用 FlexCAN_Ip_RxFifo()。 我的问题是: 在 S32K388 上,是否可以配置 eDMA TCD,使 FlexCAN 增强型 RX FIFO DMA 请求能够连续地将接收到的 FIFO 元素传输到循环 RAM 缓冲区中,而无需任何 CPU 中断或软件重新激活? 具体来说,能否使用目标模数和/或其他 eDMA TCD 功能来实现这种连续环形缓冲器? 如果可以的话,能否提供一个配置示例,或者给我推荐一个 NXP 的示例/参考实现? 如有必要,我愿意修改 RTD FlexCAN 驱动程序或直接配置 eDMA TCD。 谢谢您! Re: #S32K388 Enhanced RX FIFO + eDMA: Continuous Circular Buffer Reception Without CPU Interrupts 你好@zhangyu5454 , 该驱动程序的编写方式要求在FLEXCAN_EVENT_DMA_COMPLETE 事件中调用 FlexCAN_Ip_RxFifo() 以重新启用接收。 理论上可以实现从DMA到缓冲区的连续传输;但是,您需要修改RTD或创建自己的驱动程序。很遗憾,这超出了我们的支持范围,如果要进行此操作,则应由您自行测试其验证和功能。 您需要设置 TCDn_CSR[D_REQ] = 0 (DisAutoHwRequest = FALSE) & TCDn_CSR[INTMAJOR] 以保持通道启用并禁用中断,以及配置您的循环数据队列。您可以参考S32K3 产品页面和“安全文件”下的 S32K3 DMA 培训演示文稿。 此致, 朱利安
View full article
#S32K388 拡張RX FIFO + eDMA: CPU割り込みなしで連続循環バッファ受信 NXPサポートの皆さん、こんにちは。 私はFlexCAN Enhanced RX FIFOとRTDを搭載したS32K388を使用しています。CPU割り込みなしで連続的なDMAベースのCAN受信を実現したいと考えています。 私の要望は以下の通りです。 MCU: S32K388 CAN: クラシックキャン、CAN FD無効 CANペイロード: 8バイト FlexCAN拡張RX FIFO対応 DMA受信が有効 フィルターなしで 、どのCAN IDでもCANメッセージを受け取る必要があります。 DMAが受信したすべてのCANフレームを自動的に RAMソフトウェアのリングバッファに転送したいのです。 FlexCANの受信割り込みは不要です。 DMAのメジャーループ完了割り込みも不要です。 DMAは、CPUがFlexCAN_Ip_RxFifo()を再度呼び出すことなく、自動的に実行を継続するはずです。 理想的には、受信した各FIFO要素が即座にDMA転送を引き起こすべきなので、大きなFIFOウォーターマークを待ちたくありません。 RTDのソースコードを確認しました。FlexCAN_StartRxMessageEnhancedFifoData()で、ドライバがDMAを次のように設定していることがわかりました。 Source address = Enhanced RX FIFO output Source transfer size = 4 bytes Source offset = 4 bytes Destination transfer size = 4 bytes Destination offset = 4 bytes Minor loop size = 80 bytes Major loop count = num_enhanced_watermark EnMajorInt = TRUE DisAutoHwRequest = TRUE 現在のRTD実装では、有限のDMA転送を実行した後、停止するため、FlexCAN_Ip_RxFifo()を再度呼び出す必要があると理解しています。 私の質問は次のとおりです。 S32K388上で、eDMA TCDを設定して、FlexCAN Enhanced RX FIFO DMA要求が、CPU割り込みやソフトウェアの再武装なしに、受信したFIFO要素を円形RAMバッファに継続的に転送する設定は可能でしょうか? 特に、 Destination Modulo や他のeDMA TCD機能を使えば、この連続リングバッファを実装できますか? もし可能であれば、具体的な構成を教えていただけるか、NXPの例やリファレンス実装を教えていただけませんか? 必要に応じてRTD FlexCANドライバーを修正したり、eDMA TCDを直接設定することも可能です。 よろしくお願いします! Re: #S32K388 Enhanced RX FIFO + eDMA: Continuous Circular Buffer Reception Without CPU Interrupts こんにちは、 @zhangyu5454 さん、 ドライバーは、 FLEXCAN_EVENT_DMA_COMPLETEイベント内で受信を再アーミングするためにFlexCAN_Ip_RxFifo()を呼び出す必要があるように書かれています。 DMAからバッファへの継続的な転送は可能なはずですが、RTDを修正するか、独自のドライバを作成する必要があります。残念ながら、これは当社のサポート範囲外であり、実施する場合は検証と機能のテストをお客様に行ってください。 チャネルを起動させ、割り込みを無効にし、円形データキューを設定するには、TCDn_CSR[D_REQ] = 0 (DisAutoHwRequest = FALSE) と TCDn_CSR[INTMAJOR] を設定する必要があります。S32K3のDMAトレーニングプレゼンテーションのS32K3製品ページおよび「Secure Files」を参照してください。 よろしくお願いします、 ジュリアン
View full article
#S32K388 Enhanced RX FIFO + eDMA: Continuous Circular Buffer Reception Without CPU Interrupts Hi NXP Support, I am using an S32K388 with the FlexCAN Enhanced RX FIFO and RTD. I would like to implement a continuous DMA-based CAN reception without any CPU interrupt. My requirements are: MCU: S32K388 CAN: Classical CAN, CAN FD disabled CAN payload: 8 bytes FlexCAN Enhanced RX FIFO enabled DMA reception enabled I need to receive CAN messages with any CAN ID, without filtering. I want DMA to automatically transfer every received CAN frame into a RAM software ring buffer. I do not want a FlexCAN RX interrupt. I also do not want a DMA major-loop-complete interrupt. DMA should continue running automatically without the CPU having to call FlexCAN_Ip_RxFifo() again. Ideally, each received FIFO element should trigger a DMA transfer immediately, so I do not want to wait for a large FIFO watermark. I checked the RTD source code. In FlexCAN_StartRxMessageEnhancedFifoData(), I found that the driver configures DMA approximately as follows: Source address = Enhanced RX FIFO output Source transfer size = 4 bytes Source offset = 4 bytes Destination transfer size = 4 bytes Destination offset = 4 bytes Minor loop size = 80 bytes Major loop count = num_enhanced_watermark EnMajorInt = TRUE DisAutoHwRequest = TRUE I understand that the current RTD implementation performs a finite DMA transfer and then stops, requiring FlexCAN_Ip_RxFifo() to be called again. My question is: Is it possible on S32K388 to configure the eDMA TCD so that the FlexCAN Enhanced RX FIFO DMA request continuously transfers received FIFO elements into a circular RAM buffer, without any CPU interrupt or software re-arming? In particular, can Destination Modulo and/or another eDMA TCD feature be used to implement this continuous ring buffer? If this is possible, could you please provide an example configuration or point me to an NXP example/reference implementation? I am willing to modify the RTD FlexCAN driver or configure the eDMA TCD directly if necessary. Thanks! Re: #S32K388 Enhanced RX FIFO + eDMA: Continuous Circular Buffer Reception Without CPU Interrupts Hello @zhangyu5454, The driver is written in a way that requires FlexCAN_Ip_RxFifo() to be called in order to re-arm reception inside the FLEXCAN_EVENT_DMA_COMPLETE event. It should be possible to have a continuous transfer from DMA to buffer; however, you will need to modify the RTDs or create your own driver. Unfortunately, this is out of our support scope, and if done, verification and functionality should be tested by you. You would have to set TCDn_CSR[D_REQ] = 0 (DisAutoHwRequest = FALSE) & TCDn_CSR[INTMAJOR] in order to keep the channel armed and disable interrupts, as well as configure your circular data queue. You can refer to S32K3's DMA Training Presentation, under S32K3 Product Page and 'Secure Files'. Best regards, Julián
View full article
S32R264 – CLK_OUT0(CLKOUT)60MHzに制限がありますが、80MHzを出力できますか? #S32R2X 私はS32R264を使用しています。CLK_OUT0(図6-3はRMのMCB_CLKOUT_SELによるCLKOUTの選択を示しています)と、このピンでSDPLL_CLK80/AFEPLL_CLK80を80MHzで出力できるかどうかについて質問があります。 しかし、表5-3(「システムレベルのクロック周波数の最大値」)には、CLK_OUT[01]の最大周波数が60MHzと記載されていますが、この制限に関する説明はありません。 出力のうち1つにしかCMUが接続されていないことに気づきました。それが理由かもしれませんが、私はCMUを使用していません。 チャープ信号を生成する外部フロントエンドボードに80MHzのクロックを供給する必要があり、すべてのクロックソースを1つに絞りたいと考えています。 現在、100MHzの発振器を2台(MCU用にCWX813-040.0M、フロントエンド用にCWX813-100.0M)を使っています。良い独立発振器でも位相整列が不十分で信号品質を劣化させる可能性があると疑っています。私の波形生成は100 MHzのクロックから動作し、MCU内のAFEは40(320)MHzから動作しています。波形生成を80MHzに切り替え、そのクロックをMCUから取り入れて、システム全体を同期かつ同位相にしたいと考えています。 CMUが無効になっている場合、CLK_OUT0で80MHzを出力することは可能ですか? 60MHzという制限の本当の理由は何ですか? Re: S32R264 – CLK_OUT0 (CLKOUT) limitation to 60 MHz, can I output 80 MHz? こんにちは、 CMUは監視ブロックであり、これを無効にしても許容出力周波数が増加するとは考えられていません。SDPLL_CLK80/AFEPLL_CLK80はCLK_OUTソースとして選択可能ですが、NXPが別途確認しない限り、80MHzのクロックをCLK_OUT0にルーティングすることは、文書化された動作仕様の範囲外となります。60MHzという制限の最も可能性の高い理由は、CMUの存在ではなく、クロック出力パスと出力パッドの特性限界である。 petervlna_0-1788858593730.png よろしくお願いいたします。 ピーター
View full article
S32K314 HSE設置に関する問題 助けてください!公式デモプロジェクトをベースにHSEファームウェアインストーラを作成しましたが、2回リセットした後、HSEインストールアドレス0x007E0000にデータがありません。これはHSEのインストールが失敗したということでしょうか?S32のバージョンは3.6.8で、チップは...S32K314、RTDバージョン7.0.1 1131_0-1788767775138.png1131_0-1788767775138.png これはldファイルです。 1131_1-1788767805874.png1131_1-1788767805874.png これは書き換えられたIVTベクトルです。 1131_2-1788767830677.png1131_2-1788767830677.png 1131_3-1788767849116.png1131_3-1788767849116.png 1131_4-1788767872384.png1131_4-1788767872384.png 最後に、HSEインストールデモプロジェクトを添付しました。 回复: S32K314 HSE 安装问题 @VaneBこんにちは ご提案に従ってリンカー ファイルを修正し、ivt.c ファイルのすべてのエントリをコメントアウトしました。プログラムを 2 回再起動した後、デバッグ モードで status = Hse_Ip_GetHseStatus(0u) の状態を確認しました。ステータス値は 1001 0110 0000 でしたが、9 番目のビットが 0 だったので、HSE が正常にインストールされなかったことを示しています。さらに、バージョン情報も取得できませんでした。srvResponse = Hse_Ip_ServiceRequest(0u, u8MuChannel, &request, &pHseSrvDesc) の戻り値は 0xaa55a11e です。 次のように 1131_1-1788838145743.png1131_1-1788838145743.png 1131_2-1788838165453.png1131_2-1788838165453.png 1131_3-1788838180700.png1131_3-1788838180700.png 1131_4-1788838213520.png1131_4-1788838213520.png Re: S32K314 HSE 安装问题 こんにちは@杨工1131 いくつか気づいた点があります。 リンカファイル内のコメントによると、HSEファームウェアはブロック0に配置されるべきです。しかし、現在HSE_BINARYに割り当てられているアドレスはブロック1に属しています。次のように設定する必要があります HSE_BINARY (R) : ORIGIN = 0x00400000 PFlash領域はブロック1から開始する必要があります。 int_pflash : ORIGIN = 0x00500000, LENGTH = 0x00300000 - __HSE_CODE_SIZE /* 4096KB - __HSE_CODE_SIZE (sBAF + HSE) */ 提案として、ハードコードされたアドレスを使う代わりに、HSE_FW_ADDR を次のように定義することができます。 #define HSE_FW_ADDR (__HSE_BIN_START) 別途ivt.cファイルを作成する必要はありません。画像ベクトルテーブル構造は、 Project_Settings → Startup_Code → startup_cm7.sで既に定義されています。 IVTに関しては、S32K3xxリファレンス・マニュアル改訂版12のセクション32.5.3を参照すると、CM7_2開始住所の後に続く記述は以下の通りです。 .long 0xffffffff /* Offset 0x20: Reserved */ .long LC_CONFIG_ADDR /* Offset 0x24: Lifecycle configuration pointer */ .long CM7_3_VTOR_ADDR /* Offset 0x28: CM7_3 Start address */ .long HSE_FW_ADDR /* Offset 0x2C: Reserved */ コードについては、例と同じ構造を使っているので、その部分で問題はないと思います。 BR、VaneB 回复: S32K314 HSE 安装问题 こんにちは@杨工1131 startup_cm7.sのIVTにHSEファームウェアピンクヘッダーイメージの開始アドレスも追加しましたか?CM7_3の開始アドレスの後ですか? D-Cacheが有効になっているため、キャッシュ関連の問題を回避するために、サービス記述子、キーハンドル、入出力バッファなどのHSE関連データをすべて、適切なメモリセクションに配置することで、キャッシュ不可能なメモリ領域に強制的に格納します。例えば: hseAttrFwVersion_t __attribute__((section(".mcal_data_no_cacheable"))) gHseFwVersion = {0U}; また、Hse_Ip_Init() を呼び出さないでください。アプリケーションはまずHSEファームウェアの初期化が完了するまで、FSRのステータスビットを確認し、HSE_STATUS_INIT_OKが設定されているか確認して待つべきです。この条件が満たされるまでは、HSE(英国保健安全庁)にいかなる申請も送信してはならない。 最後に、HSEファームウェアの使用を有効にした後にMCUリセットを行いましたか?
View full article