2411764_ja-JP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2411764_ja-JP

2411764_ja-JP

S32R264 – CLK_OUT0(CLKOUT)60MHzに制限がありますが、80MHzを出力できますか?

#S32R2X

私はS32R264を使用しています。CLK_OUT0(図6-3はRMのMCB_CLKOUT_SELによるCLKOUTの選択を示しています)と、このピンでSDPLL_CLK80/AFEPLL_CLK80を80MHzで出力できるかどうかについて質問があります。

しかし、表5-3(「システムレベルのクロック周波数の最大値」)には、CLK_OUT[01]の最大周波数が60MHzと記載されていますが、この制限に関する説明はありません。

出力のうち1つにしかCMUが接続されていないことに気づきました。それが理由かもしれませんが、私はCMUを使用していません。

チャープ信号を生成する外部フロントエンドボードに80MHzのクロックを供給する必要があり、すべてのクロックソースを1つに絞りたいと考えています。

現在、100MHzの発振器を2台(MCU用にCWX813-040.0M、フロントエンド用にCWX813-100.0M)を使っています。良い独立発振器でも位相整列が不十分で信号品質を劣化させる可能性があると疑っています。私の波形生成は100 MHzのクロックから動作し、MCU内のAFEは40(320)MHzから動作しています。波形生成を80MHzに切り替え、そのクロックをMCUから取り入れて、システム全体を同期かつ同位相にしたいと考えています。

CMUが無効になっている場合、CLK_OUT0で80MHzを出力することは可能ですか?

60MHzという制限の本当の理由は何ですか?

Tags (1)
No ratings
Version history
Last update:
yesterday
Updated by: