Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
Deadtime Correction Hi NXP Community, I am looking for some clarification regarding the PWM-X deadtime correction feature. From the documentation, I understand that PWM-X can modify the PWM pulses based on the current/load condition. However, I am not clear about how the PWM pattern is generated and how the required feedback signal is connected and routed. In my application, the switches and current-sensing circuitry are external to the MCU: Is the sensed current signal expected to be connected directly to an MCU pin? Or should it first go through LPCMP and then be internally routed to PWM-X through TRGMUX or another internal connection? What is the expected signal path and configuration for this feature? I have attached an image from the NXP reference design/documentation showing the slightly decaying output waveform obtained across the load. What I am particularly trying to understand is the PWM pulse pattern used to generate this waveform. The waveform shown in the reference design is the resulting waveform at the load/power stage. However, the PWM signal generated by the MCU will pass through the gate driver and switching stage, so the PWM signal itself will not have the same shape as the waveform shown. PWM-X generated pulses → gate driver/power stage → resulting waveform across the load Specifically, I would like to understand how PWM-X determines the pulse width/duty cycle and timing required to obtain the shown output waveform, including how the deadtime correction is applied. Is there any reference design, application note, example code, or reference software where this PWM-X feature is implemented? An example showing the PWM configuration, pulse pattern, pin configuration, internal signal routing, and required external circuitry would be very helpful. FlexPWM Synchronization I also have a question regarding FlexPWM synchronization. Can the synchronization signal be generated internally by another peripheral, or does it have to originate from an external MCU pin? For example, can a signal generated by eMIOS be internally routed to the FlexPWM synchronization input? Any example or clarification regarding the internal routing/configuration would be very helpful. Thanks in advance. Best regards, Ganesh Re: Deadtime Correction Hi, The waveform shown in the reference manual is the voltage across the load during the deadtime interval. It is not a waveform generated directly by PWM_X. The shape results from the load current continuing to flow through the power-stage devices while both complementary switches are off. For S32K396, the PWM period and duty cycle are still defined by the eFlexPWM counter and VAL registers, while DTCNT0/DTCNT1 control the inserted deadtime. PWM_X is used as a feedback input for deadtime distortion measurement. The sampled PWM_X state is available through the deadtime status mechanism described in Sections 56.3.11.4-56.3.11.7, and the eCapture functionality described in Section 56.3.14 can be used to measure timing information related to these events. The deadtime correction itself is not performed automatically by the eFlexPWM hardware. Instead, the application software is expected to evaluate the PWM_X feedback information and adjust the relevant PWM timing values (VAL registers) as needed. The expected signal path is therefore: Power-stage state or current-direction detection ↓ External signal conditioning / comparator ↓ PWM_X input ↓ Deadtime status bits and/or eCapture measurements ↓ Software correction algorithm ↓ Updated PWM timing values PWM_X expects a digital signal. From the S32K396 routing options, LPCMP outputs cannot be internally connected to PWM_X through TRGMUX, therefore the required feedback signal must ultimately be provided on a pin configured as the corresponding PWM_X input. Regarding synchronization, FlexPWM synchronization is not limited to an external signal source. On S32K396, an eMIOS-generated signal can be routed and used as a FlexPWM synchronization source, allowing synchronization to be implemented entirely internally without an external connection. BR, Petr
查看全文
S32K314 HSE 安装问题 求助!我参考官方演示项目编写了HSE固件安装程序,但执行两次复位后,HSE安装地址0x007E0000处没有任何数据。这是否意味着HSE安装失败了?S32 版本为 3.6.8,芯片为 S32K314,RTD 版本为 7.0.1 1131_0-1788767775138.png1131_0-1788767775138.png 这是 ld 文件 1131_1-1788767805874.png1131_1-1788767805874.png 这是重写后的IVT向量 1131_2-1788767830677.png1131_2-1788767830677.png 1131_3-1788767849116.png1131_3-1788767849116.png 1131_4-1788767872384.png1131_4-1788767872384.png 最后,我附上我的 HSE 安装的demo项目。 回复: S32K314 HSE 安装问题 @VaneB 你好 我根据你的建议修改修改了链接器文件,并将ivt.c文件全部注释掉,重新启动程序两次过后,通过调试模式观察status = Hse_Ip_GetHseStatus(0u)的状态status的值 1001 0110 0000,但是第9位为0,说明HSE并未安装成功?而且获取不到任何版本信息,srvResponse = Hse_Ip_ServiceRequest(0u, u8MuChannel, &request, &pHseSrvDesc),srvResponse 的返回值为0xaa55a11e; 如下 1131_1-1788838145743.png1131_1-1788838145743.png 1131_2-1788838165453.png1131_2-1788838165453.png 1131_3-1788838180700.png1131_3-1788838180700.png 1131_4-1788838213520.png1131_4-1788838213520.png Re: S32K314 HSE 安装问题 嗨@杨工1131 我有几点看法: 根据链接器文件中的注释,HSE 固件应该放在 Block 0 中。但是,当前分配给 HSE_BINARY 的地址属于 Block 1。应该配置为 HSE_BINARY (R) : ORIGIN = 0x00400000 PFlash 区域应从 Block 1 开始: int_pflash : ORIGIN = 0x00500000, LENGTH = 0x00300000 - __HSE_CODE_SIZE /* 4096KB - __HSE_CODE_SIZE (sBAF + HSE) */ 建议不要使用硬编码地址,而是将 HSE_FW_ADDR 定义为: #define HSE_FW_ADDR (__HSE_BIN_START) 无需创建单独的 ivt.c 文件。图像矢量表结构已在Project_Settings → Startup_Code → startup_cm7.s中定义。 关于 IVT,如果您参考 S32K3xx 参考手册第 12 版第 32.5.3 节,CM7_2 起始地址之后的条目如下: .long 0xffffffff /* Offset 0x20: Reserved */ .long LC_CONFIG_ADDR /* Offset 0x24: Lifecycle configuration pointer */ .long CM7_3_VTOR_ADDR /* Offset 0x28: CM7_3 Start address */ .long HSE_FW_ADDR /* Offset 0x2C: Reserved */ 关于代码,我看到你使用了与示例相同的结构,所以我认为这部分不会有任何问题。 BR,VaneB 回复: S32K314 HSE 安装问题 嗨@杨工1131 你是否也在 startup_cm7.s 文件中将 HSE 固件粉色头像镜像的起始地址添加到了 IVT 中?在 CM7_3 起始地址之后? 由于启用了数据缓存,为了避免缓存相关的问题,请将所有 HSE 相关数据(例如服务描述符、键句柄和输入/输出缓冲区)强制放入不可缓存的内存区域,方法是将它们放置在适当的内存区域。例如: hseAttrFwVersion_t __attribute__((section(".mcal_data_no_cacheable"))) gHseFwVersion = {0U}; 另外,不要调用 Hse_Ip_Init()。应用程序应首先等待 HSE 固件完成初始化,方法是检查 FSR 中的状态位,并确认 HSE_STATUS_INIT_OK 已设置。在满足此条件之前,不得向 HSE 发送任何请求。 最后,启用HSE固件后,您是否执行了MCU RESET?
查看全文
死时间校正 NXP社区的各位好, 我想了解一下PWM-X 死区时间校正功能的相关情况。 根据文档,我了解到 PWM-X 可以根据电流/负载情况修改 PWM 脉冲。但是,我不清楚 PWM 模式是如何生成的,以及所需的反馈信号是如何连接和路由的。 在我的应用中,开关和电流检测电路都位于MCU外部: 感知到的电流信号是否需要直接连接到MCU引脚? 或者它应该先经过LPCMP ,然后通过TRGMUX或其他内部连接内部路由到 PWM-X? 此功能的预期信号路径和配置是什么? 我附上了一张来自 NXP 参考设计/文档的图片,显示了负载上略微衰减的输出波形。 我特别想了解的是用于生成该波形的PWM脉冲模式。 参考设计中所示的波形是负载/功率级产生的波形。但是,MCU 生成的 PWM 信号会经过栅极驱动器和开关级,因此 PWM 信号本身的形状不会与所示波形相同。 PWM-X 生成的脉冲 → 栅极驱动器/功率级 → 负载两端的最终波形 具体来说,我想了解 PWM-X 如何确定获得所示输出波形所需的脉冲宽度/占空比和定时,包括如何应用死区时间校正。 是否有任何参考设计、应用笔记、示例代码或参考软件实现了此 PWM-X 功能?提供一个示例,展示 PWM 配置、脉冲模式、引脚配置、内部信号路由和所需的外部电路,将非常有帮助。 FlexPWM同步 我还有一个关于FlexPWM同步的问题。 同步信号能否由其他外设在内部生成,还是必须来自外部MCU引脚? 例如, eMIOS生成的信号能否内部路由到 FlexPWM 同步输入? 任何关于内部路由/配置的示例或说明都将非常有帮助。 先行致谢。 此致, 象头神 Re: Deadtime Correction 您好, 参考手册中显示的波形是死区时间间隔内负载两端的电压。它不是 PWM_X 直接生成的波形。当两个互补开关都关闭时,负载电流仍然流过功率级设备,从而形成了这种形状。 对于 S32K396,PWM 周期和占空比仍然由 eFlexPWM 计数器和 VAL 寄存器定义,而 DTCNT0/DTCNT1 控制插入的死区时间。 PWM_X 用作死区时间失真测量的反馈输入。采样后的 PWM_X 状态可通过第 56.3.11.4-56.3.11.7 节中描述的死区状态机制获得,并且可以使用第 56.3.14 节中描述的 eCapture 功能来测量与这些事件相关的定时信息。 eFlexPWM硬件本身并不自动执行死区时间校正。相反,应用软件需要评估 PWM_X 反馈信息,并根据需要调整相关的 PWM 时序值(VAL 寄存器)。 因此,预期的信号路径为: 功率级状态或电流方向检测 ↓ 外部信号调理/比较器 ↓ PWM_X 输入 ↓ 死区状态位和/或 eCapture 测量 ↓ 软件校正算法 ↓ 更新后的PWM时序值 PWM_X 需要一个数字信号。从 S32K396 的布线选项来看,LPCMP 输出不能通过 TRGMUX 内部连接到 PWM_X,因此所需的反馈信号最终必须在配置为相应 PWM_X 输入的引脚上提供。 关于同步,FlexPWM 同步并不局限于外部信号源。在 S32K396 上,eMIOS 生成的信号可以被路由并用作 FlexPWM 同步源,从而无需外部连接即可完全在内部实现同步。 BR,彼得
查看全文
デッドタイム補正 こんにちは、NXPコミュニティの皆さん、 PWM-Xのデッドタイム補正機能について、いくつか説明を求めています。 ドキュメントによると、PWM-Xは電流や負荷の状態に基づいてPWMパルスを修正できると理解しています。しかし、PWMパターンがどのように生成され、必要なフィードバック信号がどのように接続・ルーティングされるのかはよくわかりません。 私のアプリケーションでは、スイッチと電流検出回路はMCUの外部にあります: 検出された電流信号は直接MCUのピンに接続される予定ですか? それとも、まずLPCMPを経由してから、 TRGMUXまたは別の内部接続を介してPWM-Xに内部的にルーティングされるべきでしょうか? この機能における想定される信号経路と構成はどのようなものですか? 負荷全体でわずか に減衰する出力波形 を示すNXPの**リファレンス・デザイン**/**ドキュメント**の画像を添付しました。 私が特に理解しようとしているのは、この波形を生成するために使用されるPWMパルスパターンです。 リファレンス・デザインに示されている波形は、負荷/電力段階での得られる波形です。しかし、MCUで生成されるPWM信号はゲートドライバとスイッチングステージを通過するため、PWM信号自体は示された波形とは異なる形状になります。 PWM-Xは負荷全体→ゲートドライバー/パワーステージ→パルスを生成し、その結果として波形を生成します 具体的には、PWM-Xが、図示された出力波形を得るために必要なパルス幅/デューティサイクルとタイミングをどのように決定するのか、また、デッドタイム補正がどのように適用されるのかを理解したいと考えています。 このPWM-X機能が実装されている リファレンスデザイン、アプリケーションノート、例コード、リファレンスソフトウェア などはありますか?PWM構成、パルスパターン、ピン配置、内部信号ルーティング、および必要な外部回路を示す例があると非常に役立ちます。 FlexPWM同期 FlexPWMの同期についても質問があります。 同期信号は他のペリフェラルから内部的に生成できるのでしょうか、それとも外部のMCUピンから発信しなければならないのでしょうか? 例えば、 eMIOS で生成された信号を内部的にFlexPWM同期入力にルーティングすることは可能でしょうか? 内部ルーティング/設定に関する例や説明があれば大変助かります。 よろしくお願いいたします。 よろしくお願いします、 ガネーシャ Re: Deadtime Correction こんにちは、 リファレンス・マニュアルに示されている波形は、デッドタイム区間中の負荷両端の電圧です。これはPWM_Xによって直接生成された波形ではありません。この形状は、両方の補完スイッチがオフの状態で負荷電流がパワーステージ装置を流れ続けるために生じます。 S32K396の場合、PWM周期とデューティサイクルは引き続きeFlexPWMカウンタとVALレジスタによって定義され、DTCNT0/DTCNT1は挿入されるデッドタイムを制御します。 PWM_Xは、デッドタイム歪み測定のためのフィードバック入力として使用されます。サンプリングされたPWM_X状態は、セクション56.3.11.4-56.3.11.7で説明されているデッドタイムステータスメカニズムを通じて利用可能であり、セクション56.3.14で説明されているeCapture機能を使ってこれらのイベント情報に関連するタイミング情報を測定できます。 デッドタイム補正自体は、eFlexPWMハードウェアによって自動的に実行されるわけではありません。代わりに、アプリケーションソフトウェアはPWM_Xフィードバック情報を評価し、必要に応じて関連するPWMタイミング値(VALレジスタ)を調整することが期待されます。 したがって、想定される信号経路は以下のとおりです。 パワーステージ状態または電流方向検出 ↓ 外部信号調整/コンパレータ ↓ PWM_X入力 ↓ デッドタイムステータスビットおよび/またはeキャプチャ測定 ↓ ソフトウェア補正アルゴリズム ↓ 更新されたPWMタイミング値 PWM_Xはデジタル信号を必要とします。S32K396ルーティングオプションからは、LPCMPの出力はTRGMUXを介して内部的にPWM_Xに接続できないため、必要なフィードバック信号は最終的に対応するPWM_X入力として設定されたピンで提供されなければなりません。 同期に関して言えば、FlexPWMの同期は外部信号源に限定されません。S32K396では、eMIOSで生成された信号をルーティングしてFlexPWM同期ソースとして使用でき、外部接続なしで完全に内部で同期を実装することが可能です。 BR、ペトル
查看全文
S32R264 – CLK_OUT0 (CLKOUT) 限制为 60 MHz,我可以输出 80 MHz 吗? #S32R2X 我使用的是S32R264。我有一个关于 CLK_OUT0 的问题(图 6-3 显示了通过 RM 中的 MCB_CLKOUT_SEL 选择 CLKOUT),以及是否可以在该引脚上以 80 MHz 的频率输出 SDPLL_CLK80/AFEPLL_CLK80。 然而,表 5-3(“最大系统级时钟频率”)指出 CLK_OUT[01] 的最大频率为 60 MHz,但没有解释此限制的原因。 我注意到只有一个输出端连接了 CMU——也许这就是原因,但我不用 CMU。 我需要为产生啁啾信号的外部前端板提供 80 MHz 的时钟信号,并且我希望所有信号都使用同一个时钟源。 目前我有两个独立的 100 MHz 振荡器(CWX813‑040.0M 用于 MCU,CWX813‑100.0M 用于前端)。我怀疑即使是性能优良的独立振荡器,也可能由于相位不一致而降低信号质量。我的波形生成器运行在 100 MHz 时钟频率下,而 MCU 内部的 AFE 运行在 40 (320) MHz 时钟频率下。我想将波形生成频率切换到 80 MHz,并从 MCU 获取该时钟信号,以便整个系统同步且同相。 如果 CMU 被禁用,是否可以在 CLK_OUT0 上输出 80 MHz 信号? 60 MHz 频率限制的真正原因是什么? Re: S32R264 – CLK_OUT0 (CLKOUT) limitation to 60 MHz, can I output 80 MHz? 你好, CMU 是一个监控模块,禁用它预计不会增加允许的输出频率。尽管 SDPLL_CLK80/AFEPLL_CLK80 可以选择作为 CLK_OUT 源,但除非 NXP 另有确认,否则将 80 MHz 时钟路由到 CLK_OUT0 将超出已记录的操作规范。60 MHz 限制的最可能原因是时钟输出路径和输出焊盘的特性限制,而不是 CMU 的存在。 petervlna_0-1788858593730.png 顺祝商祺! Peter
查看全文
S32R264 – CLK_OUT0 (CLKOUT) limitation to 60 MHz, can I output 80 MHz? #S32R2X I am using S32R264. I have a question about CLK_OUT0 (Figure 6-3 shows CLKOUT selection via MCB_CLKOUT_SEL in RM) and the possibility to output SDPLL_CLK80/AFEPLL_CLK80 at 80 MHz on this pin. However, Table 5‑3 ("Maximum system level clock frequencies") says the max frequency for CLK_OUT[01] is 60 MHz, with no explanation for this restriction. I noticed only one output has a CMU attached – maybe that's the reason, but I don't use CMU. I need to provide 80 MHz to an external Frontend board that generates Chirp, and I want a single clock source for everything. Currently I have two separate 100 MHz oscillators (CWX813‑040.0M for MCU, CWX813‑100.0M for Frontend). I suspect that even good independent oscillators may degrade signal quality due to lack of phase alignment. My waveform generation runs from the 100 MHz clock, while the AFE inside MCU runs from 40 (320) MHz. I would like to switch waveform generation to 80 MHz and take that clock from MCU, so the whole system is synchronous and in phase. Is it possible to output 80 MHz on CLK_OUT0 if CMU is disabled? What is the real reason for the 60 MHz limit? Re: S32R264 – CLK_OUT0 (CLKOUT) limitation to 60 MHz, can I output 80 MHz? Hello, The CMU is a monitoring block and disabling it is not expected to increase the allowed output frequency. Although SDPLL_CLK80/AFEPLL_CLK80 may be selectable as CLK_OUT sources, routing an 80 MHz clock to CLK_OUT0 would be outside the documented operating specification unless NXP confirms otherwise. The most likely reason for the 60 MHz restriction is the characterization limit of the clock output path and output pad, rather than the presence of the CMU. petervlna_0-1788858593730.png Best regards, Peter
查看全文
IMXRT1024でヒューズを焼損させずにHABをテストする 署名のないledのblinkyコードを使ってHAB監査API(報告状況と報告イベント情報)を実装しました。EVKボードは開いており、ヒューズも焼けていません 署名なしイメージ(CSF=0) - HABが4イベント情報で失敗 署名画像 - HAB パス0イベント情報 なので、ボードでもオープンHAB認証が実行されているのでイベント情報が見られると仮定しました。 しかし今回は同じIVT(CSF=0)でプロジェクトファームウェアを使い、同じHAB監査を実施しました 署名なし画像 - 0 イベント情報 のHABパス リードされた点滅ログ(署名なし): RVTヘッダー 0x 2002c0: tag=0xdd len=0x 038 par=0x43 HAB:RVTバージョン=0x 40305 居住区:report_status() = 0x33(HAB_FAILURE) HAB: config = 0xf0(HAB_CFG_OPEN) HAB: state = 0x66(HAB_STATE_NONSECURE) HAB: event[0], 8バイト HAB: hdr: tag=0xdb len=0x 0 8 par=0x43 HAB: status=0x33(HAB_FAILURE) reason=0x22(HAB_INV_ADDRESS) context=0x a(HAB_CTX_AUTHENTICATE) engine=0x 0(HAB_ENG_ANY) HAB: raw: db 0 8 43 33 22 a 0 HAB: event[1], 20バイト HAB: hdr: tag=0xdb len=0x 014 par=0x43 HAB: status=0x33(HAB_FAILURE) reason=0x c(HAB_INV_ASSERTION) コンテキスト=0xa0(HAB_CTX_ASSERT) engine=0x 0(HAB_ENG_ANY) HAB: raw: db 0 14 43 33 c a0 0 0 0 0 0 0 60 0 10 0 0 0 0 20 HAB: event[2], 20バイト HAB: hdr: tag=0xdb len=0x 014 par=0x43 HAB: status=0x33(HAB_FAILURE) reason=0x c(HAB_INV_ASSERTION) context=0xa0(HAB_CTX_ASSERT) engine=0x 0(HAB_ENG_ANY) HAB: raw: db 0 14 43 33 c a0 0 0 0 0 0 60 0 10 20 0 0 0 1 HAB: event[3], 20バイト HAB: hdr: tag=0xdb len=0x 014 par=0x43 HAB: status=0x33(HAB_FAILURE) reason=0x c(HAB_INV_ASSERTION) コンテキスト=0xa0(HAB_CTX_ASSERT) engine=0x 0(HAB_ENG_ANY) HAB: raw: db 0 14 43 33 c a0 0 0 0 0 0 0 60 0 20 0 0 0 4 HAB: VERDICT = 4 イベント情報 記録済み -- 上記のデコード済みフィールドを参照 私のプロジェクトファームウェア(署名なし) HAB: RVTヘッダー 0x002002c0 HAB: tag=0xdd len=0x0038 par=0x43 HAB:RVTが確認され有効 居住区:RVTバージョン=0x00040305 居住区:report_status() = 0xf0 HAB: config = 0xf0 HAB: state = 0x66 HAB: 監査イベント情報やクエリなし... HAB: report_event(idx=0) 0x33返されました(イベント情報やクエリなし) HAB: VERDICT = PASS(監査イベント情報なし) なぜ違いがあるのか Re: Test HAB on IMXRT1024 without burning fuses こんにちは、 @Abhay2080 さん。 ご連絡ありがとうございます!LED点滅コードが入っているSDK版と、画像作成に使われているSPT版の両方をいただけますか? ご辛抱いただきありがとうございます! すてきな一日を、 カン ------------------------------------------------------------------------------- 注記: この投稿があなたの質問への回答になっている場合は、「正解としてマーク」ボタンをクリックしてください。ありがとうございます! - 前回の投稿から7週間Threadをフォローしており、その後の返信は無視しています もし後で関連する質問があれば、新しいThreadを開き、閉じたThreadを参照してください。 ------------------------------------------------------------------------------- Re: Test HAB on IMXRT1024 without burning fuses これはSDKバージョンです - SDK_25_06_00_MIMXRT1024xxxxx SPTバージョン - 26.06 MCU xpresso - v25.6.136 MCU Xpressoでコンパイルした場合、LED Blinky用の署名なし画像はSPTとCST 4.0の両方で作成されます Re: Test HAB on IMXRT1024 without burning fuses こんにちは、 @Abhay2080 さん。 情報と詳細なログをありがとうございます。これは素晴らしい観察結果で、違いはIVT内のCSFポインタがゼロかゼロでないかという一点に集約されます。 HABv4が認証を決定する方法 i.MX RT10xxでは、ブートROMは認証を試みるかどうかを判断する前にIVTのCSFフィールドを確認します。 CSF = 0x00000000 (null)の場合、HABは認証を完全にスキップし、イベント情報は記録されず report_status() 0xf0 (HAB_SUCCESS)を返します。これはセキュリティ上の「合格」ではありません。認証は一度も試みられていません。 CSF = non-zero (CSF領域を指す場合):HABは認証を試みます。署名が欠落または無効の場合、失敗イベント情報が記録され、 report_status() は 0x33 (HAB_FAILURE)を返します。オープンボードの場合、これはブートを停止させません。 なぜLED点滅(署名なし)が4つの故障イベント情報を示したのか あなたのLED点滅バイナリはMCUXpresso IDEによって構築され、その後SPT(Secure Provisioning Tool)で処理されてブート可能なイメージが作成されました。「署名なし」ビルドタイプの場合でも、SPTのブートイメージパイプラインは、ゼロ以外のCSFポインタをIVTに書き込み、イメージ内にCSF領域を予約します。Boot ROMは非ゼロポインタを発見し、認証を試みましたが有効な署名データは見つからず、4つのイベントを記録しました。 イベント情報0( HAB_INV_ADDRESS / HAB_CTX_AUTHENTICATE 😞 HABは認証のために画像を探しましたが、無効なアドレスに遭遇しました。これは空のCSF領域と一致します。 イベント情報1–3( HAB_INV_ASSERTION / HAB_CTX_ASSERT 😞 HABによる画像領域に対する内部検証は、実際の脳脊髄液データが存在しないため失敗しました。 なぜプロジェクトのファームウェア(署名なし)にイベント情報が0と表示されたのか あなたのプロジェクトファームウェアは、SPTの起動可能なイメージ生成ステップ を経ずに 、MCUXpresso IDEを通じて直接コンパイルされました。結果として得られるバイナリには、IVT内に真のヌルCSFポインタが含まれています。Boot ROMは CSF = 0 を認識し、認証を完全にスキップし、HABはクリーンな報告をします。ログの report_event(idx=0) からの 0x33 リターンは「このインデックスにイベント情報なし」(つまり、クエリ自体が何も保存されていないため返HAB_FAILURE)を意味しており、HABが故障を検出したわけではありません。 確認の簡単な方法 バイトオフセット +0x18 (CSFフィールド)で、両方のバイナリのIVTを調べます。 SPT製LED点滅:ゼロ以外の値(例: 0x60006xxx または類似のフラッシュアドレス) プロジェクトファームウェア: 0x00000000 プロジェクトのファームウェアで HAB 監査を適切にテストするには 起動可能なイメージはSPT(またはelftosb/nxpimage)でビルドし、CSF領域をイメージに埋め込む必要があります。署名なしビルドでも同様です。これにより、Boot ROMが認証を試み、HABイベント情報が生成されます。そうして初めて、HAB監査コードはテスト目的のための有意義なデータを収集できるようになります。 まとめると、HAB認証はオープンボード上で動作するというあなたの最初の仮定は正しいですが、それはIVTに非ゼロのCSFポインタが存在する場合に限られます。プロジェクトのファームウェアで観察された動作は想定どおりであり、正しいものです。 これで少しでも分かりやすくなれば幸いです!他に質問があればお知らせください。   すてきな一日を、 カン ------------------------------------------------------------------------------- 注記: この投稿があなたの質問への回答になっている場合は、「正解としてマーク」ボタンをクリックしてください。ありがとうございます! - 前回の投稿から7週間Threadをフォローしており、その後の返信は無視しています もし後で関連する質問があれば、新しいThreadを開き、閉じたThreadを参照してください。 ------------------------------------------------------------------------------- Re: Test HAB on IMXRT1024 without burning fuses はい、Kan_Liあなたが言った説明は正しいですが、正しいシナリオは私たちにとってです。 LED点滅(署名なし)-> このバイナリiはMCU Xpresso IDEのみで生成(SPT経由は処理していません)。サイズ - 30KB そして、LED点滅(符号なし)と私のプロジェクト(符号なし)の両方のIVTを比較しても、両方ともまったく同じIVT(CSF=0)でした。サイズ 64KB 16進数比較を参照 左側はLED点滅、右側は私のプロジェクトのファームウェアです また、ヒューズを焼損させずにHABを正しくテストする方法についても教えてください。 Abhay2080_0-1788931301704.pngAbhay2080_0-1788931301704.pngAbhay2080_0-1788931301704.pngAbhay2080_0-1788931301704.png Re: Test HAB on IMXRT1024 without burning fuses こんにちは、 @Abhay2080 さん。 16進数での比較をありがとうございます。おかげで状況がずっと分かりやすくなりました。おっしゃる通り、両方のバイナリはCSF=0の同一のIVT(初期値変換)を持っています。実際の根本原因は、CSFポインタではなく、ブートデータ size フィールドにあります。 16進ダンプの内容 ファイルオフセット 0x1020 (IVTの boot_data が指す位置)にあるブートデータ構造を見てみましょう。 フィールド LED点滅 プロジェクトファームウェア start (0x1020) 0x60000000 0x60000000 size (0x1024) 0x00004000 = 16 KB 0x00000400 = 1 KB plugin (0x1028) 0x00000000 0x00000000 IVT内の両方のCSFフィールドは 0x00000000 であり、同一であることが確認されました。 HABの挙動が異なる理由 HABライブラリの authenticate_image() は、認証を試みる前に画像スコープを決定するために、Boot Data領域( start から start + size )を使用します。重要なことに、 IVT自体はフラッシュオフセット 0x1000 (ベースから4096バイト)に配置されています。HABは、IVTが宣言されたブートデータ領域内に含まれるかどうかを確認します。 LED点滅— ブートデータは16KB( 0x4000 )を宣言します。オフセット 0x1000 (4096)のIVTは [0x60000000, 0x60004000) の中にあります。HAB は IVT を見つけ、 authenticate_image() を試行し、CSF=0 に遭遇します → ログには HAB_INV_ADDRESS + 3 つのアサーション失敗が記録されます → report_status() = HAB_FAILURE 。 プロジェクトファームウェア- ブートデータは 1 KB ( 0x400 ) のみを宣言しています。オフセット 0x1000 (4096)のIVTは [0x60000000, 0x60000400) 外側です。HABは宣言された領域内で有効なIVTを検出できず→認証は→ report_status() = HAB_SUCCESS , 0イベント情報で完全にスキップされます。 まとめると、プロジェクトファームウェアの1KBブートデータサイズは誤って小さすぎます。IVTはその境界を超えているため、HABはそれに手を出しません。 ブートデータのサイズはどちらも、実際のバイナリファイルのサイズ(それぞれ30KBと64KB)とは一致しないことに注意してください。両方のイメージは、適切なブート可能なイメージビルダーではなく、IDEが直接生成したブートデータを持っています。サイズのずれの程度によって、HABが発生するかどうかが決まります。 根本的な原因 SPTやelftosbを経ずにMCUXpresso IDEから直接コンパイルすると、結果として得られるバイナリはHAB評価のための適切なブートデータ構造を持ちません。 size フィールドは、IVT を包含する場合と包含しない場合がある値に設定され、予測不可能な HAB 監査結果をもたらします。 ヒューズを焼損させずにHABを正しくテストする方法 オープンボードにおける信頼できる手法は以下のとおりです。 SPTまたはelftosbを使用してビルドします。これにより、ブートデータ(ベースからCSF/コードの終わりまでイメージ全体をカバーする start 、 size )、FCB、IVT、およびオプションでCSFブロックが正しく設定されます。生のIDEコンパイル .bin でHABをテストするのは絶対に避けてください。ブートデータは信頼性が低くなります。 署名のないイメージ(CSF=0、正しいブートデータ)でテスト してください — HABは認証を試みますがCSFは検出できず、 HAB_INV_ADDRESS +アサーション失敗を記録します。 report_status() = HAB_FAILURE 。これにより、HABが正しく動作しており、監査コードが正常に機能していることが確認できます。これはまさに、あなたのLED点滅+SPTの結果が示していたことと同じです。 署名付きイメージ(CSFが有効で、ブートデータが正しいもの)を使用してテストします。SPTまたはCST 4.0を使用して、キーで適切に署名されたイメージを作成します。オープンボードでは、HABは埋め込まれたSRK/CSFを使用してイメージを認証します。署名が有効であれば、→ report_status() = HAB_SUCCESS 、0のイベント情報となります。署名が間違っていたり欠如している場合、→失敗のイベント情報。どちらの場合もオープンボード上でブートが続きます。 ヒューズを書き込む前に信頼性を確認してください。署名済みのイメージがオープンボードに表示され、HAB_SUCCESS が表示された後でのみ、SRK ハッシュヒューズを書き込んでください。これにより認証チェーン全体が安全に検証されます。 推奨されるテスト手順(すべてオープンボードで実施): Step 1: SPT -> Build unsigned image -> Flash -> Run HAB audit Expected: HAB_FAILURE, 4 events (HAB is running, audit code is correct) Step 2: SPT/CST -> Build signed image -> Flash -> Run HAB audit Expected: HAB_SUCCESS, 0 events (signing + authentication working end-to-end) Step 3: Corrupt the signed image or swap keys -> Flash -> Run HAB audit Expected: HAB_FAILURE, events logged (confirms rejection logic) Step 4: Burn fuses (SRK hash) -> confirm Step 2 still passes on Closed board これで違いが十分に説明できたでしょうか。重要なポイントは、HABをテストする際は必ずSPT/elftosbを使って起動可能なイメージを構築することです。生のIDEバイナリは使わないでください。 すてきな一日を、 カン ------------------------------------------------------------------------------- 注記: この投稿があなたの質問への回答になっている場合は、「正解としてマーク」ボタンをクリックしてください。ありがとうございます! - 前回の投稿から7週間Threadをフォローしており、その後の返信は無視しています もし後で関連する質問があれば、新しいThreadを開き、閉じたThreadを参照してください。 ------------------------------------------------------------------------------- Re: Test HAB on IMXRT1024 without burning fuses @Kan_Li 、Boot データは小さなエンディアン32ビットワードに保存されているため、両方のバイナリのStartは同じなので、誤解されていると思います 始め0x60000000 ブートデータサイズは LED点滅 - 0x00400000(4MB) 私のプロジェクトです - 0x00040000(256KB) つまり、あなたの説明通りIVTは定義されたブートデータ内に含まれます Re: Test HAB on IMXRT1024 without burning fuses こんにちは、 @Abhay2080 さん。 おっしゃる通りです。バイト順序の誤りについてお詫び申し上げます。両方のブートデータサイズ(4MBと256KB)にはIVTが含まれているため、以前の説明は誤りでした。 根本原因:スタートアップコードによってHABイベントログが消去された ブートROMは両方のイメージに対して同じ4つの失敗イベント情報(CSF=0、認証試行)を生成します。違いは、プロジェクトファームウェアのCランタイム起動時が、HABライブラリがイベントログやステータスを保存する領域を含む大きなOCRAM領域をゼロにし、HAB監査コードが実行される 前に ゼロ化することです。そのため、 report_status() は 0xF0 返却し、イベント情報は0でした。HAB状態自体が消去されたのです。 修正方法: HAB監査コールをBSSのゼロイニットループの前に Reset_Handler に移動すると、イベント情報が見えます。 他に何かご質問がありましたら、お気軽にお知らせください。 すてきな一日を、 カン ------------------------------------------------------------------------------- 注記: この投稿があなたの質問への回答になっている場合は、「正解としてマーク」ボタンをクリックしてください。ありがとうございます! - 前回の投稿から7週間Threadをフォローしており、その後の返信は無視しています もし後で関連する質問があれば、新しいThreadを開き、閉じたThreadを参照してください。 -------------------------------------------------------------------------------
查看全文
CIRサンプル・トゥ・タップ・インデックス・マッピングおよびSR150におけるファーストパス後のセカンダリーピークに関する質問 こんにちは、 私は以下のデバイス、SDK、ファームウェアを使用しています。 ・対象デバイス:村田製作所製 2BP EVK型(NXP Trimension SR150) ・SDKバージョン:v05.11.05 ・ファームウェア:PNP_RhodesV4_SE_v05.11.05.bin SR150から取得したCIRデータに関して、2つ質問があります。 1. CIRサンプルとタップ指数の関係 SR150から取得された16のCIRサンプルと対応するTap Indexとの関係について、説明していただけますか? 私の理解では、16個のCIRサンプル(cir[0]からcir[15]まで)には、それらの絶対タップインデックスを直接示す情報は含まれていません。 cir[0]に対応するタップインデックスを特定する方法、または計算式はありますか? また、診断情報で利用可能なファーストパスインデックスと配列インデックスcir[0]からcir[15]との関係についても理解したいと思っています。 例えば、CIRサンプリングウィンドウがFirst Path Indexを基準に決定される場合、First Path Index cir[0]の前後に何タップが対応しているかを知りたいです。 2. 第一道の直後に観測された二次峰 CIRを調べる中で、検出された第一経路の約3〜4サンプル後に比較的明確な二次ピークが現れるケースを観察しています。 添付図は、この動作の一例を示しています。 この例では、主要なCIRピークはタップインデックス834付近で観測され、別の局所的なピークは、約3タップ後のタップインデックス837付近で現れます。図中の赤い円で示されているのが、二次ピークである。 20260907.png この二次ピークの可能な原因を説明していただけますか? 特に、これはSR150の内部相関器処理による既知または予想される応答、例えば送信・受信パルスの自己相関特性や相関応答のサイドローブなどである可能性はありますか? サポートにあらかじめ感謝いたします。 よろしくお願いいたします。 Re: Questions about CIR Sample-to-Tap Index Mapping and Secondary Peak after First Path on SR150 こんにちは、@Ricardo_Zamora さん。 ご回答とSR150のサポート経路の明確化に感謝します。 詳細な情報はNDAの下で公開できないことを理解しています。 これらの技術的な質問については、適切なモジュールパートナーまたは直接の担当者に連絡します。 改めて、サポートとご指導に感謝いたします。 よろしくお願いいたします。 Re: Questions about CIR Sample-to-Tap Index Mapping and Secondary Peak after First Path on SR150 こんにちは、 あなたの調子が良いといいのですが。ご不便をおかけして申し訳ありませんが、この製品の情報はNDA(秘密保持契約)に基づいており、公開されていません。 チップについての詳細は、代理店ネットワークで利用可能な当社の代理店のいずれかにお問い合わせください。NXPですか?または、このデバイスを手に入れるのを手伝った直接の連絡先がいれば、ぜひ連絡してください。 もし当社のUWB製品に関する情報をお探しの方やこのテクノロジに興味がある方は、パートナー(Trimension UWB Partners)のこれらの開発キットとモジュールをご確認いただくことをお勧めします。 これらのキットやモジュールに興味がある場合は、直接彼らに相談してプロセスやサポートを受けられるかを知る必要があります。なぜなら、このテクノロジのサポートは彼らを通じて行われるからです。 ドキュメントとソフトウェアは対応するUWBモジュールパートナーによって配布されます。モジュールを選択すると、パートナーのページに案内され、データシート、アプリケーションノート、必要なイネーブルメントにアクセスできます よろしくお願いいたします。 リカルド
查看全文
Test HAB on IMXRT1024 without burning fuses I have taken unsigned led blinky code and implemented HAB audit API (report status and report event). EVK board is open and fuses not burnt Unsigned image(CSF=0) - HAB fail with 4 events Signed image - HAB pass 0 events  So i assumed that even board is open HAB authentication runs and hence i can see events. But now i taken project firmware with same IVT (CSF=0) and i implemented same HAB audit but this time Unsigned image - HAB pass with 0 events Led blinky logs (unsigned): RVT header at 0x 2002c0: tag=0xdd len=0x 038 par=0x43 HAB: RVT version = 0x 40305 HAB: report_status() = 0x33(HAB_FAILURE) HAB: config = 0xf0(HAB_CFG_OPEN) HAB: state = 0x66(HAB_STATE_NONSECURE) HAB: event[0], 8 bytes HAB: hdr: tag=0xdb len=0x 0 8 par=0x43 HAB: status=0x33(HAB_FAILURE) reason=0x22(HAB_INV_ADDRESS) context=0x a(HAB_CTX_AUTHENTICATE) engine=0x 0(HAB_ENG_ANY) HAB: raw: db 0 8 43 33 22 a 0 HAB: event[1], 20 bytes HAB: hdr: tag=0xdb len=0x 014 par=0x43 HAB: status=0x33(HAB_FAILURE) reason=0x c(HAB_INV_ASSERTION) context=0xa0(HAB_CTX_ASSERT) engine=0x 0(HAB_ENG_ANY) HAB: raw: db 0 14 43 33 c a0 0 0 0 0 0 60 0 10 0 0 0 0 20 HAB: event[2], 20 bytes HAB: hdr: tag=0xdb len=0x 014 par=0x43 HAB: status=0x33(HAB_FAILURE) reason=0x c(HAB_INV_ASSERTION) context=0xa0(HAB_CTX_ASSERT) engine=0x 0(HAB_ENG_ANY) HAB: raw: db 0 14 43 33 c a0 0 0 0 0 0 60 0 10 20 0 0 0 1 HAB: event[3], 20 bytes HAB: hdr: tag=0xdb len=0x 014 par=0x43 HAB: status=0x33(HAB_FAILURE) reason=0x c(HAB_INV_ASSERTION) context=0xa0(HAB_CTX_ASSERT) engine=0x 0(HAB_ENG_ANY) HAB: raw: db 0 14 43 33 c a0 0 0 0 0 0 60 0 20 0 0 0 0 4 HAB: VERDICT = 4 EVENT(S) LOGGED -- see decoded fields above but  my  project firmware(unsigned) HAB: RVT header at 0x002002c0 HAB: tag=0xdd len=0x0038 par=0x43 HAB: RVT found and valid HAB: RVT version = 0x00040305 HAB: report_status() = 0xf0 HAB: config = 0xf0 HAB: state = 0x66 HAB: querying audit events... HAB: report_event(idx=0) returned 0x33 (no events or query HAB: VERDICT = PASS (no audit events logged) Why there is a difference  Re: Test HAB on IMXRT1024 without burning fuses Hi @Abhay2080 , Thanks for the reaching out! May I have the sdk version that has the led blinky code and the SPT version used for building the image?  Thank for your patience! Have a great day, Kan ------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "Mark Correct" button. Thank you! - We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. ------------------------------------------------------------------------------- Re: Test HAB on IMXRT1024 without burning fuses This is SDK version - SDK_25_06_00_MIMXRT1024xxxxx SPT version - 26.06 MCU xpresso - v25.6.136 unsigned image for led blinky if compiled through mcu xpresso and then signed image is created through both SPT and CST 4.0 Re: Test HAB on IMXRT1024 without burning fuses Hi @Abhay2080 , Thanks for the info and detailed logs — this is a great observation and the difference comes down to one thing: whether the CSF pointer in the IVT is zero or non-zero. How HABv4 decides to authenticate On i.MX RT10xx, the Boot ROM checks the CSF field of the IVT before deciding whether to attempt authentication: If CSF = 0x00000000 (null): HAB skips authentication entirely — no events are logged and report_status() returns 0xf0 (HAB_SUCCESS). This is not a "pass" in the security sense; authentication was never attempted. If CSF = non-zero (points to a CSF region): HAB attempts authentication — if the signature is missing or invalid, failure events are logged and report_status() returns 0x33 (HAB_FAILURE). On an open board this does not halt boot. Why your LED blinky (unsigned) showed 4 failure events Your LED blinky binary was built by MCUXpresso IDE and then processed through SPT (Secure Provisioning Tool) to create a bootable image. Even for an "unsigned" build type, SPT's bootable image pipeline writes a non-zero CSF pointer into the IVT and reserves a CSF region in the image. The Boot ROM found that non-zero pointer, attempted authentication, found no valid signature data, and logged the 4 events: Event 0 ( HAB_INV_ADDRESS / HAB_CTX_AUTHENTICATE 😞 HAB tried to locate the image for authentication but encountered an invalid address — consistent with an empty/stub CSF region. Events 1–3 ( HAB_INV_ASSERTION / HAB_CTX_ASSERT 😞 HAB's internal assertion checks on the image regions failed because there is no real CSF data present. Why your project firmware (unsigned) showed 0 events Your project firmware was compiled directly through MCUXpresso IDE without going through SPT's bootable image generation step. The resulting binary has a genuinely null CSF pointer in the IVT. The Boot ROM sees CSF = 0 , skips authentication entirely, and HAB reports clean. The 0x33 return from report_event(idx=0) in your log means "no event at this index" (i.e., the query itself returns HAB_FAILURE because there is nothing stored), not that HAB detected a failure. Quick way to verify Inspect the IVT of both binaries at byte offset +0x18 (the CSF field): SPT-built LED blinky: non-zero value (e.g., 0x60006xxx or similar flash address) Your project firmware: 0x00000000 To properly test HAB audit with your project firmware You need to build the bootable image through SPT (or elftosb/nxpimage) so that a CSF region is embedded in the image — even for an unsigned build. This ensures the Boot ROM attempts authentication and HAB events are generated. Only then will your HAB audit code capture meaningful data for testing purposes. In summary, your original assumption is correct that HAB authentication runs on an open board — but only when a non-zero CSF pointer is present in the IVT. The behavior you observed with your project firmware is expected and correct. Hope this helps clarify! Let us know if you have further questions.   Have a great day, Kan ------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "Mark Correct" button. Thank you! - We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. ------------------------------------------------------------------------------- Re: Test HAB on IMXRT1024 without burning fuses Yes Kan_Li the explaination you mentioned is correct but the correct scenario us - LED blinky (unsigned) -> This binary i generated through MCU xpresso IDE only (not processed through SPT). size - 30KB And even i compare the IVT for both led blinky unsigned and my project unsigned both have exactly same IVT (CSF=0) .- size 64KB See hex compare left side is Led blinky and right side is my project firmware Also please mention what is the right way to test HAB without burning fuses Abhay2080_0-1788931301704.pngAbhay2080_0-1788931301704.pngAbhay2080_0-1788931301704.pngAbhay2080_0-1788931301704.png Re: Test HAB on IMXRT1024 without burning fuses Hi @Abhay2080 , Thank you for the hex comparison — this gives a much clearer picture. You're correct that both binaries have identical IVTs with CSF=0. The actual root cause is in the Boot Data size field, not the CSF pointer. What the hex dump shows Looking at the Boot Data structure at file offset 0x1020 (pointed to by boot_data in the IVT): Field LED Blinky Project Firmware start (0x1020) 0x60000000 0x60000000 size (0x1024) 0x00004000 = 16 KB 0x00000400 = 1 KB plugin (0x1028) 0x00000000 0x00000000 Both CSF fields in the IVT are 0x00000000 — confirmed identical. Why the HAB behavior differs The HAB library's authenticate_image() uses the Boot Data region ( start to start + size ) to determine the image scope before attempting authentication. Crucially, the IVT itself is located at flash offset 0x1000 (= 4096 bytes from base). HAB checks whether the IVT falls within the declared Boot Data region: LED Blinky — Boot Data declares 16 KB ( 0x4000 ). IVT at offset 0x1000 (4096) is inside [0x60000000, 0x60004000) . HAB finds the IVT, attempts authenticate_image() , encounters CSF=0 → logs HAB_INV_ADDRESS + 3 assertion failures → report_status() = HAB_FAILURE . Project Firmware — Boot Data declares only 1 KB ( 0x400 ). IVT at offset 0x1000 (4096) is outside [0x60000000, 0x60000400) . HAB cannot locate a valid IVT within the declared region → authentication is skipped entirely → report_status() = HAB_SUCCESS , 0 events. In summary: the 1 KB Boot Data size in your project firmware is incorrectly too small — the IVT sits beyond that boundary, so HAB never touches it. Note that neither Boot Data size matches the actual binary file sizes (30 KB and 64 KB respectively). Both images have Boot Data that was generated by the IDE directly rather than through a proper bootable image builder. The difference in how wrong the size is determines whether HAB engages. Root cause When you compile directly from MCUXpresso IDE without going through SPT or elftosb, the resulting binary does not have a properly formed Boot Data structure for HAB evaluation. The size field ends up set to a value that may or may not encompass the IVT, giving unpredictable HAB audit results. The correct way to test HAB without burning fuses The reliable methodology on an Open board is: Build through SPT or elftosb — this correctly populates the Boot Data ( start , size covering the entire image from base to end of CSF/code), FCB, IVT, and optionally the CSF block. Never test HAB using a raw IDE-compiled .bin — the Boot Data will be unreliable. Test with an unsigned image (CSF=0, correct Boot Data) — HAB will attempt authentication, find no CSF, and log HAB_INV_ADDRESS + assertion failures. report_status() = HAB_FAILURE . This confirms HAB is running correctly and your audit code is working. This is exactly what your LED blinky + SPT result showed. Test with a signed image (CSF valid, correct Boot Data) — build a properly signed image via SPT or CST 4.0 with your keys. On an Open board, HAB authenticates the image with the embedded SRK/CSF. If the signature is valid → report_status() = HAB_SUCCESS , 0 events. If the signature is wrong or absent → failure events. Boot continues in both cases on an Open board. Confidence check before burning fuses — only after you see HAB_SUCCESS with your signed image on an Open board should you proceed to burn the SRK hash fuses. This validates the entire authentication chain safely. Recommended test sequence (all on Open board): Step 1: SPT -> Build unsigned image -> Flash -> Run HAB audit Expected: HAB_FAILURE, 4 events (HAB is running, audit code is correct) Step 2: SPT/CST -> Build signed image -> Flash -> Run HAB audit Expected: HAB_SUCCESS, 0 events (signing + authentication working end-to-end) Step 3: Corrupt the signed image or swap keys -> Flash -> Run HAB audit Expected: HAB_FAILURE, events logged (confirms rejection logic) Step 4: Burn fuses (SRK hash) -> confirm Step 2 still passes on Closed board Hope this fully explains the difference. The key takeaway is to always use SPT/elftosb for building the bootable image when testing HAB — never the raw IDE binary. Have a great day, Kan ------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "Mark Correct" button. Thank you! - We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. ------------------------------------------------------------------------------- Re: Test HAB on IMXRT1024 without burning fuses @Kan_Li i think you misunderstood since Boot data is stored in little Endian 32-bit word, So Start in both binaries are same Start 0x60000000 Boot data size is LED blinky - 0x00400000 (4MB) My project it is - 0x00040000 (256KB) So as per your explanation IVT falls inside the defined boot data Re: Test HAB on IMXRT1024 without burning fuses Hi @Abhay2080 , You're right — apologies for the byte order error. Both Boot Data sizes (4 MB and 256 KB) include the IVT, so my previous explanation was incorrect. Root cause: HAB event log cleared by startup code The Boot ROM generates the same 4 failure events for both images (CSF=0, authentication attempted). The difference is that your project firmware's C runtime startup zeroes a larger OCRAM region — which includes the area where the HAB library stores its event log and status — before your HAB audit code runs. This is why report_status() returns 0xF0 and 0 events are found; the HAB state itself was wiped. How To Fix: Move your HAB audit calls to Reset_Handler , before the BSS zero-init loop, and the events will be visible. Please kindly let me know if you have any further question. Have a great day, Kan ------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "Mark Correct" button. Thank you! - We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. -------------------------------------------------------------------------------
查看全文
关于 SR150 上 CIR 样品到抽头索引映射和第一路径后次峰的问题 您好, 我使用的设备、SDK 和固件如下: ・目标设备:村田 Type 2BP EVK(NXP Trimension SR150) ・SDK 版本:v05.11.05 ・固件:PNP_RhodesV4_SE_v05.11.05.bin 关于从 SR150 获得的 CIR 数据,我有两个问题。 1. CIR 样品与敲击指数的关系 请您解释一下从 SR150 获得的 16 个 CIR 样本与相应的 Tap Index 之间的关系? 据我了解,16 个 CIR 样本(cir[0] 到 cir[15])不包含直接指示其绝对 Tap Index 的信息。 是否有方法或公式来确定哪个 Tap Index 对应于 circ[0]? 我还想了解诊断信息中可用的第一路径索引与数组索引 cir[0] 到 cir[15] 之间的关系。 例如,如果 CIR 采样窗口是相对于第一路径索引确定的,我想知道第一路径索引 cir[0] 之前或之后有多少个抽头。 2. 在第一条路径之后不久观察到的次峰 在检查 CIR 时,我观察到一些案例,在检测到的第一路径之后大约 3-4 个样本(TAP)处出现了一个相对明显的次峰。 附图展示了这种行为的一个例子。 在这个例子中,主要的 CIR 峰值出现在 Tap Index 834 附近,而另一个局部峰值出现在 Tap Index 837 附近,大约在 3 taps 之后。图中红色圆圈标出了次峰。 20260907.png 请问您能否解释一下造成这个次峰的可能原因? 具体来说,这是否可能是 SR150 内部相关器处理引起的已知或预期响应,例如发射/接收脉冲的自相关特性或相关响应的旁瓣? 感谢您提前给予的支持。 顺祝商祺! Re: Questions about CIR Sample-to-Tap Index Mapping and Secondary Peak after First Path on SR150 嗨@Ricardo_Zamora , 感谢您的回复,并感谢您澄清了SR150的支持途径。 我明白详细信息受保密协议约束,不能公开分享。 我会联系相应的模块合作伙伴或我们的直接联系人来解答这些技术问题。 再次感谢您的支持和指导。 顺祝商祺! Re: Questions about CIR Sample-to-Tap Index Mapping and Secondary Peak after First Path on SR150 你好, 希望你一切都好。很抱歉给您带来不便,但由于该产品的信息受保密协议(NDA)约束,因此不对外公开。 如需了解有关该芯片的更多信息,请联系我们代理商网络|NXP中的一位代理商。或者,如果您有任何直接联系人曾帮助您获得此设备,请与他们联系。 如果您正在寻找有关我们 UWB 产品的信息,或者您对这项技术感兴趣,我建议您查看我们合作伙伴( Trimension UWB 合作伙伴)提供的这些开发套件和模块。 如果您对这些套件/模块感兴趣,您需要直接与他们联系,了解流程以及他们能够提供的支持,因为这项技术的支持途径是通过他们。 文档和软件由相应的UWB模块合作伙伴分发。选择模块后,您将被引导至我们合作伙伴的页面,您可以在该页面访问数据表、应用笔记和所需的启用信息。 此致, 里卡多
查看全文
Questions about CIR Sample-to-Tap Index Mapping and Secondary Peak after First Path on SR150 Hi, I am using the following device, SDK, and firmware: ・Target device: Murata Type 2BP EVK (NXP Trimension SR150) ・SDK version: v05.11.05 ・Firmware: PNP_RhodesV4_SE_v05.11.05.bin I have two questions regarding the CIR data obtained from the SR150. 1. Relationship between CIR samples and Tap Index Could you please clarify the relationship between the 16 CIR samples obtained from the SR150 and the corresponding Tap Index? As I understand it, the 16 CIR samples, cir[0] through cir[15], do not contain information that directly indicates their absolute Tap Index. Is there a way, or a formula, to determine which Tap Index corresponds to cir[0]? I would also like to understand the relationship between the First Path Index available in the diagnostic information and the array indices cir[0] through cir[15]. For example, if the CIR sampling window is determined relative to the First Path Index, I would like to know how many taps before or after the First Path Index cir[0] corresponds to. 2. Secondary peak observed shortly after the First Path When examining the CIR, I have observed cases where a relatively distinct secondary peak appears approximately 3–4 samples (taps) after the detected First Path. The attached figure shows an example of this behavior. In this example, the main CIR peak is observed around Tap Index 834, while another local peak appears around Tap Index 837, approximately 3 taps later. The secondary peak is highlighted by the red circle in the figure. 20260907.png Could you please clarify the possible cause of this secondary peak? In particular, could this be a known or expected response caused by the SR150's internal correlator processing, such as the autocorrelation characteristics of the transmitted/received pulse or sidelobes of the correlation response? Thank you in advance for your support. Best regards, Re: Questions about CIR Sample-to-Tap Index Mapping and Secondary Peak after First Path on SR150 Hi @Ricardo_Zamora, Thank you for your response and for clarifying the support path for the SR150. I understand that the detailed information is under NDA and cannot be shared publicly. I will contact the appropriate module partner or our direct contact regarding these technical questions. Thank you again for your support and guidance. Best regards, Re: Questions about CIR Sample-to-Tap Index Mapping and Secondary Peak after First Path on SR150 Hello, Hope you are doing well. Sorry for the inconvenience this might cause you but as the information of this product it's under NDA (Non-Disclosure Agreement) the information it's not public. For more information about the chip could you please contact one of our distributors available in the Distributor Network|NXP? Or if you have any direct contact who helped you getting this device, please contact them. If you are looking for information about our UWB products or you are interested in this technology, I would recommend you check these Development Kits and Modules from our Partners (Trimension UWB Partners). In case you are interested in one of these Kits/Modules, you would need to go directly with them to know the process and the support that they can provide them, as the support path for this technology is through them. The documentation and software are distributed by the corresponding UWB Module partner. By selecting a module, you will be guided to our partner’s page where you can access datasheets, application notes, and the required enablement Regards, Ricardo
查看全文
在不烧断熔丝的情况下测试 IMXRT1024 上的 HAB 功能 我使用了未签名的 LED 闪烁代码,并实现了 HAB 审计 API(报告状态和报告事件)。EVK板开路,熔丝未烧断。 无符号镜像(CSF=0)- HAB 失败,共发生 4 个事件 签名图像 - HAB 通过 0 事件 所以我假设即使板处于打开状态,HAB 认证也会运行,因此我可以看到事件。 但是现在我使用了相同的 IVT (CSF=0) 项目固件,并实施了相同的 HAB 审计,但这次是 未签名图像 - HAB 通过,事件数为 0 LED闪烁日志(未签名) : RVT 标头位于 0x2002c0:标签=0xdd 长度=0x038 参数=0x43 HAB:RVT 版本 = 0x 40305 HAB:report_status() = 0x33(HAB_FAILURE) HAB:配置 = 0xf0(HAB_CFG_OPEN) HAB:状态 = 0x66(HAB_STATE_NONSECURE) HAB:事件[0],8 字节 HAB:hdr:标签=0xdb 长度=0x08 参数=0x43 HAB:状态=0x33(HAB_FAILURE) 原因=0x22(HAB_INV_ADDRESS) 上下文=0xa(HAB_CTX_AUTHENTICATE) 引擎=0x0(HAB_ENG_ANY) HAB:原始数据:db 0 8 43 33 22 a 0 HAB:事件[1],20 字节 HAB:hdr:标签=0xdb 长度=0x014 参数=0x43 HAB:状态=0x33(HAB_FAILURE) 原因=0xc(HAB_INV_ASSERTION) 上下文=0xa0(HAB_CTX_ASSERT) 引擎=0x0(HAB_ENG_ANY) HAB:原始数据:db 0 14 43 33 c a0 0 0 0 0 0 60 0 10 0 0 0 0 20 HAB:事件[2],20 字节 HAB:hdr:标签=0xdb 长度=0x014 参数=0x43 HAB:状态=0x33(HAB_FAILURE) 原因=0xc(HAB_INV_ASSERTION) 上下文=0xa0(HAB_CTX_ASSERT) 引擎=0x0(HAB_ENG_ANY) HAB:原始数据:db 0 14 43 33 c a0 0 0 0 0 0 60 0 10 20 0 0 0 1 HAB:事件[3],20 字节 HAB:hdr:标签=0xdb 长度=0x014 参数=0x43 HAB:状态=0x33(HAB_FAILURE) 原因=0xc(HAB_INV_ASSERTION) 上下文=0xa0(HAB_CTX_ASSERT) 引擎=0x0(HAB_ENG_ANY) HAB:原始数据:db 0 14 43 33 c a0 0 0 0 0 0 60 0 20 0 0 0 0 4 HAB:结果 = 4 个事件已记录 -- 请参阅上面的解码字段,但 我的项目固件(未签名) HAB:RVT 标头位于 0x002002c0 HAB:标签=0xdd 长度=0x0038 参数=0x43 HAB:RVT已找到且有效 HAB:RVT 版本 = 0x00040305 HAB:report_status() = 0xf0 HAB:配置 = 0xf0 HAB:状态 = 0x66 HAB:正在查询审计事件... HAB:report_event(idx=0) 返回 0x33(无事件或查询) HAB:结果 = 通过(未记录任何审计事件) 为什么会有差异 Re: Test HAB on IMXRT1024 without burning fuses 你好@Abhay2080 , 感谢您的联系!请问能否提供包含LED 闪烁代码的 SDK 版本以及用于构建镜像的 SPT 版本? 感谢您的耐心等待! 祝你有美好的一天, 坎 ------------------------------------------------------------------------------- 笔记: - 如果此回复解答了您的问题,请点击“标记为正确答案”按钮。谢谢你! - 我们会持续关注帖子,从最后一条回复发出后持续7周,之后的回复将被忽略。 如果您之后有相关问题,请另开新帖并引用已关闭的帖子。 ------------------------------------------------------------------------------- Re: Test HAB on IMXRT1024 without burning fuses 这是 SDK 版本 - SDK_25_06_00_MIMXRT1024xxxxx SPT 版本 - 26.06 MCU xpresso - v25.6.136 如果使用 MCU Xpresso 编译,则 LED 闪烁灯的未签名镜像;如果使用 SPT 和 CST 4.0 编译,则生成的是已签名镜像。 Re: Test HAB on IMXRT1024 without burning fuses 你好@Abhay2080 , 感谢您提供的信息和详细日志——这是一个很棒的观察,区别归根结底在于一件事: IVT 中的 CSF 指针是零还是非零。 HABv4 如何决定进行身份验证 在 i.MX RT10xx 上,启动 ROM 会检查 IVT 的 CSF 字段,然后再决定是否尝试进行身份验证: 如果 CSF = 0x00000000 (null):HAB完全跳过身份验证——不记录任何事件,并且 report_status() 返回 0xf0 (HAB_SUCCESS)。从网络安全意义上讲,这并非“通行证”;从未尝试进行身份验证。 如果 CSF = non-zero (指向 CSF 区域):HAB尝试进行身份验证——如果签名缺失或无效,则会记录失败事件,并且 report_status() 返回 0x33 (HAB_FAILURE)。在开放式电路板上,这不会阻止启动。 为什么您的 LED 指示灯(未签名)显示 4 个故障事件 您的 LED 闪烁二进制文件由 MCUXpresso IDE 构建,然后通过 SPT(安全配置工具)处理以创建可启动映像。即使对于“无符号”版本类型,SPT 的可引导映像管道也会将非零 CSF 指针写入IVT,并在映像中保留一个 CSF 区域。启动 ROM 检测到非零指针,尝试进行身份验证,但未找到有效的签名数据,并记录了以下 4 个事件: 事件 0 ( HAB_INV_ADDRESS / HAB_CTX_AUTHENTICATE 😞 HAB 尝试查找用于身份验证的图像,但遇到了无效地址——这与空/短截线 CSF 区域一致。 事件 1–3 ( HAB_INV_ASSERTION / HAB_CTX_ASSERT 😞 由于没有真正的脑脊液数据,HAB 对图像区域的内部断言检查失败了。 为什么您的项目固件(未签名)显示 0 个事件 您的项目固件直接通过 MCUXpresso IDE 编译,而没有经过 SPT 的可启动映像生成步骤。生成的二进制文件中,IVT 的CSF 指针确实为空。启动 ROM 检测到 CSF = 0 ,完全跳过身份验证,HAB 报告干净。日志中 report_event(idx=0) 返回的 0x33 表示“此索引处没有事件”(即,查询本身返回 HAB_FAILURE,因为没有存储任何内容),而不是 HAB 检测到了故障。 快速验证方法 检查两个二进制文件在字节偏移量 +0x18 处的 IVT(CSF 字段): SPT内置LED闪烁:非零值(例如, 0x60006xxx 或类似的闪存地址) 您的项目固件: 0x00000000 要使用您的项目固件正确测试 HAB 审计 您需要通过 SPT(或 elftosb/nxpimage)构建可引导映像,以便将 CSF 区域嵌入映像中——即使对于未签名的构建也是如此。这样可以确保启动 ROM 尝试进行身份验证并生成 HAB 事件。只有这样,您的 HAB 审计代码才能捕获用于测试目的的有意义的数据。 总而言之,你最初的假设是正确的,即 HAB 认证是在开放的板上运行的——但仅当 IVT 中存在非零的 CSF 指针时才如此。您观察到的项目固件的行为是预期的,也是正确的。 希望这能有所帮助!如果您还有其他问题,请与我们联系。   祝你有美好的一天, 坎 ------------------------------------------------------------------------------- 笔记: - 如果此回复解答了您的问题,请点击“标记为正确答案”按钮。谢谢你! - 我们会持续关注帖子,从最后一条回复发出后持续7周,之后的回复将被忽略。 如果您之后有相关问题,请另开新帖并引用已关闭的帖子。 ------------------------------------------------------------------------------- Re: Test HAB on IMXRT1024 without burning fuses 是的,Kan_Li,你提到的解释是正确的,但正确的场景是—— LED 闪烁(无符号)-> 此二进制文件仅通过 MCU xpresso IDE 生成(未通过 SPT 处理)。大小 - 30KB 即使我比较了 LED 闪烁(无符号)和我的项目(无符号)的 IVT,它们的 IVT 也完全相同(CSF=0)。大小 64KB 参见十六进制比较 左侧是 LED 闪烁灯,右侧是我的项目固件。 另外,请问在不烧断熔丝的情况下测试HAB的正确方法是什么? Abhay2080_0-1788931301704.pngAbhay2080_0-1788931301704.pngAbhay2080_0-1788931301704.pngAbhay2080_0-1788931301704.png Re: Test HAB on IMXRT1024 without burning fuses 你好@Abhay2080 , 感谢您提供的十六进制对比图——这让情况变得清晰多了。你说得对,这两个二进制文件都具有相同的 IVT,CSF=0。真正的根本原因在于启动数据 size 字段,而不是 CSF 指针。 十六进制转储显示的内容 查看文件偏移量 0x1020 处的启动数据结构(在 IVT 中由 boot_data 指向): 字段 LED闪烁灯 项目固件 start (0x1020) 0x60000000 0x60000000 size (0x1024) 0x00004000 = 16 KB 0x00000400 = 1 KB plugin (0x1028) 0x00000000 0x00000000 IVT 中的两个 CSF 场均为 0x00000000 — 已确认相同。 为什么有害藻华的行为会有所不同 HAB 库的 authenticate_image() 使用启动数据区域( start 到 start + size )来确定映像范围,然后再尝试进行身份验证。关键在于, IVT 本身位于闪存偏移量 0x1000 (= 从基址算起 4096 字节) 。HAB 检查 IVT 是否位于已声明的启动数据区域内: LED 闪烁— 启动数据声明 16 KB ( 0x4000 )。偏移量 0x1000 (4096) 处的 IVT 位于 [0x60000000, 0x60004000) 内。HAB 找到 IVT,尝试 authenticate_image() ,遇到 CSF=0 → 记录 HAB_INV_ADDRESS + 3 个断言失败 → report_status() = HAB_FAILURE 。 项目固件— 启动数据仅声明 1 KB ( 0x400 )。偏移量 0x1000 (4096) 处的 IVT 位于 [0x60000000, 0x60000400) 之外。HAB 无法在声明的区域内找到有效的 IVT →完全跳过身份验证 → report_status() = HAB_SUCCESS ,0 个事件。 总结一下:你的项目固件中的 1 KB 启动数据大小太小了——IVT 超出了该边界,因此 HAB 永远不会触及它。 请注意,启动数据的大小与实际二进制文件的大小(分别为 30 KB 和 64 KB)不符。这两个镜像的启动数据都是由 IDE 直接生成的,而不是通过正规的启动镜像生成器生成的。尺寸误差的程度决定了有害藻华是否会发生。 根本原因 如果直接从 MCUXpresso IDE 编译而不经过 SPT 或 elftosb,则生成的二进制文件没有用于 HAB 评估的正确格式的启动数据结构。 size 字段最终被设置为一个可能包含也可能不包含 IVT 的值,从而导致 HAB 审核结果不可预测。 不烧断熔丝测试HAB的正确方法 在开放板中,可靠的方法是: 通过 SPT 或 elftosb 构建——这将正确填充启动数据( start 、 size ,涵盖从基础到 CSF/代码末尾的整个映像)、FCB、IVT,以及可选的 CSF 块。切勿使用原始的 IDE 编译的 .bin 测试 HAB – 启动数据将不可靠。 使用未签名映像进行测试(CSF=0,正确的启动数据) — HAB 将尝试进行身份验证,找不到 CSF,并记录 HAB_INV_ADDRESS + 断言失败。 report_status() = HAB_FAILURE 。这证实了 HAB 运行正常,并且您的审计代码有效。这与你的 LED 闪烁 + SPT 测试结果完全一致。 使用签名镜像进行测试(CSF 有效,正确的启动数据) — 构建一个正确签名的镜像通过 SPT 或 CST 4.0 使用您的密钥。在 Open 板上,HAB 使用嵌入式 SRK/CSF 对映像进行认证。如果签名有效 → report_status() = HAB_SUCCESS ,0 个事件。如果签名错误或缺失 → 发生故障事件。在两种情况下,Open 板上的启动过程都会继续进行。 在烧毁熔丝之前进行置信度检查——只有在 Open 板上看到带有签名映像的 HAB_SUCCESS 后,才能继续烧毁 SRK 哈希熔丝。这样可以安全地验证整个身份验证链。 推荐测试顺序(全部在 Open 板上进行): Step 1: SPT -> Build unsigned image -> Flash -> Run HAB audit Expected: HAB_FAILURE, 4 events (HAB is running, audit code is correct) Step 2: SPT/CST -> Build signed image -> Flash -> Run HAB audit Expected: HAB_SUCCESS, 0 events (signing + authentication working end-to-end) Step 3: Corrupt the signed image or swap keys -> Flash -> Run HAB audit Expected: HAB_FAILURE, events logged (confirms rejection logic) Step 4: Burn fuses (SRK hash) -> confirm Step 2 still passes on Closed board 希望这能彻底解释清楚二者的区别。关键在于,在测试 HAB 时,始终使用 SPT/elftosb 构建可启动映像,而绝不能使用原始 IDE 二进制文件。 祝你有美好的一天, 坎 ------------------------------------------------------------------------------- 笔记: - 如果此回复解答了您的问题,请点击“标记为正确答案”按钮。谢谢你! - 我们会持续关注帖子,从最后一条回复发出后持续7周,之后的回复将被忽略。 如果您之后有相关问题,请另开新帖并引用已关闭的帖子。 ------------------------------------------------------------------------------- Re: Test HAB on IMXRT1024 without burning fuses @Kan_Li我觉得你误解了,因为启动数据是以小端序 32 位字存储的,所以两个二进制文件中的起始位置是相同的。 起始地址 0x60000000 启动数据大小为 LED闪烁 - 0x00400000 (4MB) 我的项目文件大小为 - 0x00040000 (256KB) 所以根据你的解释,IVT 属于已定义的启动数据范围。 Re: Test HAB on IMXRT1024 without burning fuses 你好@Abhay2080 , 你说得对——很抱歉出现了字节顺序错误。两种启动数据大小(4 MB 和 256 KB)都包含 IVT,所以我之前的解释是错误的。 根本原因:HAB 事件日志被启动代码清除 Boot ROM 为两个映像生成相同的 4 个故障事件(CSF=0,尝试身份验证)。区别在于,你的项目固件的 C 运行时启动会在 HAB 审计代码运行之前,将一个更大的 OCRAM 区域(包括 HAB 库存储其事件日志和状态的区域)清零。这就是为什么 report_status() 返回 0xF0 且未找到任何事件;HAB 状态本身已被清除。 解决方法:将 HAB 审计调用移至 Reset_Handler ,在 BSS 零初始化循环之前,事件就会可见。 如果您还有其他问题,请随时告诉我。 祝你有美好的一天, 坎 ------------------------------------------------------------------------------- 笔记: - 如果此回复解答了您的问题,请点击“标记为正确答案”按钮。谢谢你! - 我们会持续关注帖子,从最后一条回复发出后持续7周,之后的回复将被忽略。 如果您之后有相关问题,请另开新帖并引用已关闭的帖子。 -------------------------------------------------------------------------------
查看全文
[SPSDK][i.MX95] nxpele 读取公共熔丝失败 您好, 我正在研究如何在 IMX95 19x19 EVK 板上启用安全启动。我已经使用 SPSDK 成功对我的镜像进行了签名。现在,在写入熔丝之前,我想使用 `nxpele` 读取它们,但我遇到了以下错误。 ``` $ nxpele -f mimx9596 -d uboot_serial -p /dev/ttyUSB2 read-common-熔丝 --index 136 SPSDK解析错误:SPSDK:响应中的消息大小无效:0x4 请查看调试日志文件:/home/user/.local/state/spsdk/3.11.0/log/debug.log 获取更多信息 ``` 日志中显示以下内容: ``` $ tail -60 /home/user/.local/state/spsdk/3.11.0/log/debug.log raise SPSDKParsingError(f"响应中的消息 SIZE 无效:{hex(size)}") spsdk.exceptions.SPSDKParsingError: SPSDK: 响应中的消息大小无效: 0x4 调试:spsdk:***************************************************(自启动以来已耗时 206 毫秒,spsdk_logger.py:212) DEBUG:spsdk:* SPSDK 调试日志记录已启动 2026-09-03 15:58:44 * (自启动以来耗时 207 毫秒,spsdk_logger.py:213) 调试信息:spsdk:* SPSDK 版本:3.11.0* (自启动以来耗时 207 毫秒,spsdk_logger.py:215) 调试信息:spsdk:* Python 版本:3.14.4* (自启动以来耗时 207 毫秒,spsdk_logger.py:216) 调试:spsdk:* 操作系统版本:Linux-6.12.95+deb13-amd64-x86_64-with-glibc2.43 * (自启动以来耗时 208 毫秒,spsdk_logger.py:217) DEBUG:spsdk:* 最后一条命令:['/usr/bin/../lib/spsdk/bin/nxpele', '-f', 'mimx9596', '-d', 'uboot_serial', '-p', '/dev/ttyUSB2', 'read-common-熔丝', '--index', '136'] * (自启动以来已过去 208 毫秒,spsdk_logger.py:218) 调试:spsdk:***************************************************(自启动以来已运行 208 毫秒,spsdk_logger.py:219) 跟踪:spsdk.uboot.uboot:Uboot写入 -> 无效(自开始以来已耗时 210 毫秒, __init__ .py:50) 调试:spsdk.uboot.uboot:Uboot读取直到 <- => (自启动以来已过去 210 毫秒,uboot.py:271) 调试:spsdk.uboot.uboot:正在检查如果串口控制台因发送无效命令而打开:“无效\r\n未知命令‘无效’ - 请尝试‘帮助’\r\nu-boot=>”(自启动以来 224 毫秒,uboot.py:209) 调试:spsdk.utils.database:当前数据库指纹哈希值:f0f0598d4e6ae6c755d693693f232e30537cfb3b(自启动以来耗时 226 毫秒,database.py:1967) 调试信息:spsdk.utils.database:已加载从缓存读取数据库:/tmp/spsdk-cache-1001/spsdk/3.11.0/db_data_25a661a55aac_3.11.0.cache(自启动以来耗时 226 毫秒,database.py:1976) 调试:spsdk.utils.misc:正在加载从 /usr/lib/spsdk/lib/python3.14/site-packages/spsdk/data/devices/mimx9596/database.yaml 读取文本文件(自启动以来耗时 226 毫秒,misc.py:312) 信息:spsdk.ele.ele_comm:ELE通信器在 mimx9596 中使用 92800000 地址处的 196608 B 大小的缓冲区,版本:最新目标。 调试:spsdk.ele.ele_comm:ELE消息 0x92800000 0x30000 0602971788000000 (自启动以来已过去 245 毫秒,ele_comm.py:502) 跟踪:spsdk.uboot.uboot:Uboot写入 -> ele_message 0x92800000 0x30000 0602971788000000 (自开始以来耗时 246 毫秒, __init__ .py:50) 调试:spsdk.uboot.uboot:Uboot读取直到 <- => (自启动以来 246 毫秒,uboot.py:271) 调试:spsdk.ele.ele_comm:原始ELE消息输出: ele_message 0x92800000 0x30000 0602971788000000 060497e1d60000000000000000000200u-boot=> (自启动以来 256 毫秒,ele_comm.py:422) 调试:spsdk.ele.ele_comm:已剥离输出:060497e1d600000000000000(自启动以来耗时 256 毫秒,ele_comm.py:460) 调试:spsdk.apps.utils.utils:SPSDK:响应中的消息大小无效:0x4(自启动以来耗时 257 毫秒,utils.py:182) 回溯(最近一次调用): 文件“/usr/lib/spsdk/lib/python3.14/site-packages/spsdk/apps/utils/utils.py”,第 172 行,包装纸 retval = function(*args, **kwargs) 文件“/usr/lib/spsdk/lib/python3.14/site-packages/spsdk/apps/nxpele.py”,在 safe_main 函数的第 2189 行 sys.exit(main()) # pylint: disable=no-value-for-parameter ~~~~^^ 文件“/usr/lib/spsdk/lib/python3.14/site-packages/click/core.py”,第 1631 行,在__call__ 返回 self.main(*args,**kwargs) ~~~~~~~~~^^^^^^^^^^^^^^^^^ 文件“/usr/lib/spsdk/lib/python3.14/site-packages/click/core.py”,第 1552 行,主线 rv = self.invoke(ctx) 文件“/usr/lib/spsdk/lib/python3.14/site-packages/click/core.py”,第 2032 行,在 invoke 中 返回 _process_result(sub_ctx.command.invoke(sub_ctx)) ~~~~~~~~~~~~~~~~~~~~~~^^^^^^^^^ 文件“/usr/lib/spsdk/lib/python3.14/site-packages/click/core.py”,第 1415 行,在 invoke 中 返回 ctx.invoke(self.callback,**ctx.params) ~~~~~~~~~~^^^^^^^^^^^^^^^^^^^^^^^^^^^^^ 文件“/usr/lib/spsdk/lib/python3.14/site-packages/click/core.py”,第 910 行,在 invoke 中 返回回调函数(*args, **kwargs) 文件“/usr/lib/spsdk/lib/python3.14/site-packages/click/decorators.py”,第 46 行,在 new_func 中 返回 f(get_current_context().obj, *args, **kwargs) 文件“/usr/lib/spsdk/lib/python3.14/site-packages/spsdk/apps/nxpele.py”,第 575 行,在 cmd_read_common_fuse 中 ele_read_common_fuse(handler, index) ~~~~~~~~~~~~~~~~~~~~^^^^^^^^^^^^^^^^ 文件“/usr/lib/spsdk/lib/python3.14/site-packages/spsdk/apps/nxpele.py”,第 588 行,在 ele_read_common_fuse 中 ele_handler.send_message(read_common_fuse_msg) ~~~~~~~~~~~~~~~~~~~~~~~~^^^^^^^^^^^^^^^^^^^^^^ 文件“/usr/lib/spsdk/lib/python3.14/site-packages/spsdk/ele/ele_comm.py”,第 519 行,在 send_message 函数中 msg.decode_response(response) ~~~~~~~~~~~~~~~~~~~^^^^^^^^^^ 文件“/usr/lib/spsdk/lib/python3.14/site-packages/spsdk/ele/ele_message.py”,第 1235 行,在 decode_response 中 super().decode_response(response) ~~~~~~~~~~~~~~~~~~~~~~~^^^^^^^^^^ 文件“/usr/lib/spsdk/lib/python3.14/site-packages/spsdk/ele/ele_message.py”,第 346 行,在 decode_response 中 raise SPSDKParsingError(f"响应中的消息 SIZE 无效:{hex(size)}") spsdk.exceptions.SPSDKParsingError: SPSDK: 响应中的消息大小无效: 0x4 ``` 注:我使用的是 `SPSDK 3.11.0` 我已在 SPSDK 的 GitHub 页面上创建了一个 issue: https://github.com/nxp-mcuxpresso/spsdk/issues/116#issue-5346231614 非常感谢您的帮助。 谢谢! BR, Re: [SPSDK][i.MX95] nxpele read-common-fuse fails 嗨joanxie 我使用的是 Linux 电路板支持包 版本 LF6.18.20_2.0.0 (yocto wrynose) 以下是 nxpele get-info 的输出结果 $ nxpele -f mimx9596 -d uboot_serial -p /dev/ttyUSB2 get-info ELE get info ends successfully: Command: 0xda Version: 4 Length: 256 SoC ID: SocId:Unknown_0x9590 - 0x9590 SoC version: B000 Life Cycle: OEM_OPEN - 0x0010 SSSM state: 4 Attest API version: 0 UUID: bc193865d65e45f193b55cc234303a0f SHA256 ROM PATCH: d5d2cdc98cb54b64bffb00687edcd994ebfdd762275a66a858d928ae2fcff494 SHA256 FW: 525f972dbb772acd9f461bfc148d29beb5dc2f2e9693ff1b9ace182a8ffd8131 Advanced information: OEM SRKH: 0000000000000000000000000000000000000000000000000000000000000000 CSAL state: EdgeLock secure enclave random context initialization succeed - 0x02 TRNG state: TRNG entropy is valid and ready to be read - 0x03 OEM PQC SRKH: 00000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000 Re: [SPSDK][i.MX95] nxpele read-common-fuse fails 请问您执行此命令时使用的是哪个 EL 固件版本?让我再确认一下。 Re: [SPSDK][i.MX95] nxpele read-common-fuse fails 我重现了这个问题,并检查了内部数据库,确认这是一个已存在的问题,将在 spsdk 3.12.0 中修复。
查看全文
i.MX RT1176 – FlexIO2パラレル受信:達成可能な最大シフトクロックは?わずか約48 MSPSしか到達しなかった iMXR1176 SDK 25.09.00 Manifest 3.15.0 ゴール i.MX RT1176に搭載されているLTC2164 16ビットADCからデータを取得しています。データパスは次のとおりです。 LTC2164(フルレートCMOS出力)→FlexIO2(パラレルRX)→eDMA→外部SDRAM ハードウェアのセットアップ LTC2164フルレートCMOS出力モードで構成され、外部100MHz発振器(100MSPS、16ビット並列)でクロックされます。 ADCデータ出力D0–D15はGPIO_AD_00...GPIO_AD_15。 ADC CLKOUT+はGPIO_AD_30に接続され、FlexIOタイマークロック(外部ピンクロックソース)として使用されました。 ソフトウェアのセットアップ FlexIO2は並列レシーバとして構成され、データはシフター7にラッチされます。シフター7から>0は、DMA要求が主張される前に32バイトバッファリングされるようにチェーンされています。 kDmaRequestMuxFlexIO2Request0Request1によってトリガーされたeDMAは、ピンポン(スキャッター/ギャザー)モードで2つのTCDを使用します。各メジャーループ完了時、つまり16384サンプルごとに割り込みが発生します。 FlexIO2の機能クロック:120MHz。 バスクロック(eDMA/SEMC側):240MHz。 問題 100 MSPS の場合、16384 サンプルの処理には163.84 µsかかるはずです。連続する 2 つの DMA 割り込み間の時間を測定 (GPIO トグル + オシロスコープ) すると、常に338 µsという結果が得られ、これは約 2.06 倍です。 これは約48 MSPSの実効持続レートに相当し、ボトルネックはADCやSDRAMではなくFlexIO側にあることを示唆している。 質問 RT1176の並列受信モードにおけるFlexIOの最大シフトクロック周波数に関する公式な文書はありますか?RMやデータシートにはそのような数値は見つかりませんでした。 タイマークロックのソースが外部ピンの場合、FlexIOの機能クロックと外部シフトクロックの比率はどのようになりますか?私のFlexIOクロック(120MHz)は、入力される100MHzクロックのわずか1.2倍ですが、それで十分でしょうか?それとも、入力同期ロジックには2倍または4倍が必要ですか? ほぼ正確な×2の比率を考えると、これはFlexIOタイマーがクロックの両端で減少している(TIMMPの慣例)によるもので、タイマー比較値が実質的にスループットを半分に減らしているのではないでしょうか? この部分でのFlexIO + eDMAの最大現実的な持続スループットについてのガイダンスがあれば、非常に助かります。なぜなら、別のペリフェラルに移行するか外部FIFOに切り替えるかを判断するからです。 よろしくお願いいたします。 通信・制御(I3C |I2C |SPI |FlexCAN |イーサネット |FlexIO) Re: i.MX RT1176 – FlexIO2 parallel receive: maximum achievable shift clock? Only ~48 MSPS reached こんにちは、ご返信ありがとうございます。確かに望ましい性能は達成できましたが、Flexioペリフェラルの推奨クロック周波数を最大を超えたことでしかできませんでした。具体的には、120MHzでクロックを設定するのではなく、100MSpsの取得には200MHz以上のクロック速度が必要ですが、120MHz構成ではクロックエッジがミスされます。問題は、200 MHzで動作しているにもかかわらず(リファレンスマニュアルには最大120 MHzと記載されていますが)、温度条件や生産バッチごとに安定して動作する保証がないことです。 Re: i.MX RT1176 – FlexIO2 parallel receive: maximum achievable shift clock? Only ~48 MSPS reached こんにちは、@azed38 さん。 外部ピンをクロックソースとして使用した場合、わずかな同期レイテンシが発生することに注意してください。RMのセクション67.3.3.2によると、このレイテンシは0.5から1.5 FlexIOクロックサイクルの範囲です。 Habib_MS_1-1788818202534.pngHabib_MS_1-1788818202534.pngHabib_MS_1-1788818202534.png FlexIOとDMAで達成可能な最大スループットに関しては、FlexIOとDMAの性能テストは存在しません。しかし AN12686 、FlexIOとDMAを用いた並列通信実装を示しているため、あなたのユースケースに関連する指針となるかもしれません。 BR ハビブ Re: i.MX RT1176 – FlexIO2 parallel receive: maximum achievable shift clock? Only ~48 MSPS reached こんにちは、@azed38 さん。 このトピックに関してはすでに別のチャネルでサポートを受けているのに気づきましたので、すべてのコミュニケーションを集中管理するために引き続きサポートを続けます。FlexIOを最大周波数仕様を超えて運用すると、最終アプリケーションに影響を与える予期せぬ挙動を引き起こす可能性があることを付け加えたいと思います。RMの表15-4「クロックルート」に記載されている情報に基づき、最大周波数を120MHzにすることを推奨します。 BR ハビブ Re: i.MX RT1176 – FlexIO2 parallel receive: maximum achievable shift clock? Only ~48 MSPS reached こんにちは、 この問題は、セクション「67.3.3.2」で説明されているピン同期の遅延が原因である可能性が高い。「ピン同期」というリファレンスマニュアルの内容です。 前述の構成を考慮すると、問題の根本原因は、このモジュールのピン同期遅延に起因する、入力データ周波数とFlexIOの動作クロック周波数の比率にある。 例えば、ピン同期遅延が存在するため、SPI MasterのようなFlexIOエミュレート**ペリフェラル**は、FlexIO動作クロック周波数の最大ボーレートでしか動作できません。RMの67.4.3節に記載されているように:「同期遅延のため、シリアル入力データのセットアップ時間は1.5 FlexIOクロックサイクルとなり、最大ボーレートはFlexIOクロック周波数の4で割られます。」 この場合、スループットは減少することが予想されており、ピン同期遅延はFlexIOモジュール固有の動作であるため、回避策はありません。 このため、FlexIOモジュールの適切な動作を保証するための最大動作周波数が120MHzであることと相まって、RT1170では期待される100MSPSは実現できません。 BR ハビブ Re: i.MX RT1176 – FlexIO2 parallel receive: maximum achievable shift clock? Only ~48 MSPS reached > ほぼ正確な ×2 比率を踏まえると、これはFlexIOタイマーがクロックの両端で減少していること(TIMCMPの慣例)によるもので、タイマー比較値が実質的にスループットを半分に減らしているのではないでしょうか? 念のため申し上げておきますが、FlexIOタイマーは、ピンまたはトリガーからクロック供給されている場合、デュアルエッジ検出に対応しています。つまり、外部信号が上昇エッジと下降エッジを1つだけ作った場合、タイマーは比較値に2回カウントされます。 また、これまでのFlexIOの一般的な経験から言うと、外部信号はFlexIOのクロックレートの半分までしか扱えないと思います。他にどうやって二重エッジを感知できるのでしょうか?エッジを検出するためには、クロック周期ごとに外部ピンを2回サンプリングする必要がある。
查看全文
MCXW727CMFTBT — 出厂空白设备上的 SWD 连接失败(2 台设备,故障相同) 我们无法与任何MCXW727CMFTBT 样品(2 个单元,定制板)建立 SWD 调试连接,而完全相同的探针/电缆/设置却能立即连接到其他方面完全相同的板(相同的原理图,相同的物料清单,只有 MCU 不同)上的 MCXW716C。 元件: MCXW727CMFTBT,HVQFN-48封装,日期代码9D2604,批号PF2R73.00;板:定制PCB(10引脚Cortex调试SWD,无ISP按钮),出厂空白/从未编程; SDK: MCUXpresso SDK 26.06.00 — 应用程序构建/链接正常,故障仅在调试连接阶段出现。 症状 使用 NXP LinkServer 25.12.83 和正版 SEGGER J-Link Plus 均出现完全相同的故障:   LinkServer: Error: Wire Ack Fault - target connected? Ed:02: Failed on connect: Ee(42). No connection to chip's debug port J-Link: device MCXW727C_M33_0 / connect (VTref correctly read at 3.025V) ERROR: Wrong DM-AP IDCODE detected: 0xFFFFFFFF LinkServer 自身的 MCXW7XX 预连接脚本 (LS_preconnect_MCXW7XX.scp) 会自动发出调试会话请求 — 但仍然失败。nxpdebugmbox (SPSDK) 手动启动调试会话也失败,出现相同的 WIRE ACK FAULT 错误。 已经排除 探头/电缆/适配器:已确认工作正常(同样的配置连接到MCXW716C也没问题) MCU 端的 VDD_IO / P3V3:~3.3V,正确 SWDIO/SWDCLK 连续性:良好 VDD_CORE(内部 低压差线性稳压器(LDO)):1.065V,在范围内 RESET_b 处于静止状态,电缆拔出:读取0V而不是预期的内部上拉 ~3.3V(参考)。手册第22.3.1节)— 两个单元 连接尝试期间,强制外部将 RESET_b 设置为 3.3V(VTref 读取正确为 3.025V):无变化,仍然失败,并出现相同的错误:DM-AP IDCODE 错误 0xFFFFFFFF 在两台独立的物理设备/两块独立的电路板上均可复现。 相关帖子 这里报告了完全相同的错误(DM-AP IDCODE 0xFFFFFFFF),设备名称相同,但情况不同(板卡工作正常,但在擦除/重新编程周期后损坏): FRDM-MCXW72 不再连接。我们的设备从未进行过任何刷机,因此如果像该帖子所暗示的那样与 NBU/核心状态有关联,那么它显然也会影响客户从未触碰过的设备。 问题 对于早期生产的 MCXW727CMFTBT(批号 PF2R73.00),是否存在任何已知的勘误/启动配置要求/默认生命周期状态,导致在标准调试邮箱程序之外的空白设备上阻止 SWD 操作? 两个单元的 RESET_b 在静止状态下读数均为 0V(与文档中记录的内部上拉电阻相反)——是该批次产品的制造问题,还是上电时会有其他因素驱动该引脚? 针对这种情况,有没有不需要基于UART的ISP(我们的板子没有板载USB-UART桥接器)的推荐恢复方法? 乐意根据要求提供完整日志、示波器捕获或其他任何有用的信息。 协议:BLE -> 连接性 协议:Thread Re: MCXW727CMFTBT — SWD connection fails on factory-blank devices (2 units, identical failure) 感谢您的快速跟进! 为了澄清,我们使用两种探针分别进行了测试,每种探针都使用各自合适的工具——没有将 LinkServer 与 J-Link 探针混用: NXP MCU-Link Pro ,通过LinkServer 25.12.83访问,通过 MCUXpresso for VS Code 调试/闪存集成(它会在底层启动 LinkServer 的 gdbserver/flash-programmer)。这是我们日常的正常工作安排。 结果:线路确认故障 - 目标已连接?/ Ed:02: 连接失败: Ee(42)。无法连接到芯片的调试端口,即使 LinkServer 自动运行其 MCXW7XX 特定的预连接脚本(LS_preconnect_MCXW7XX.scp,该脚本会发出调试会话请求)时也是如此。 一个独立的、正品的SEGGER J-Link Plus (固件 V11.00)+ J-Link Adapter CortexM(20 针 → 10 针 0.05 英寸),通过J-Link Commander V9.74直接访问(而不是通过 LinkServer)。 结果:错误:检测到错误的 DM-AP IDCODE:连接时为 0xFFFFFFFF,VTref 已正确读取为 3.025 V。 我们专门进行了第二次测试,以排除任何 LinkServer/MCU-Link 特有的问题。使用完全相同的 J-Link Plus + 适配器 + 电缆 + 实验室电源设置,仅将目标板更换为我们的 MCXW716C 型号(PCB 相同,只有 MCU 不同), J-Link Commander 连接成功并识别出 Cortex-M33 内核——因此确认探针、电缆、适配器和工具工作正常;故障似乎是 MCXW727C 部件/板特有的。 我们还没有专门尝试过 J-Flash 或 LinkFlash,只尝试过 J-Link Commander(连接)和 LinkServer 的内置“调试”和“恢复”闪存编程器模式——如果这有助于进一步缩小问题范围,我们很乐意尝试其中任何一个。 与我们联系,如果需要提供任何其他信息或日志。 顺祝商祺! Re: MCXW727CMFTBT — SWD connection fails on factory-blank devices (2 units, identical failure) 你好@Rwaka ,希望你一切都好。 为了更好地了解您观察到的现象,请您确认一下,在每种情况下,您是否都使用了外部 J-Link 调试器?或者您是否也尝试过使用 MCU-Link Pro? 此外,请提供您用于通过 SWD 访问的工具(LinkFlash、J-Flash、J-Link Commander),因为 Linkserver 是用于启动和管理 NXP 调试探针的 GDB 服务器的实用程序(例如,因此,MCU-Link Pro),预计 Linkserver 不会检测到 J-Link 探针。J-Link Plus 探针只能与 J-Link Commander/J-Flash 工具一起被检测到和使用。 Re: MCXW727CMFTBT — SWD connection fails on factory-blank devices (2 units, identical failure) 你好@Rwaka ,感谢你提供补充信息。 我注意到您提到 Reset_b 信号读数为 0V,这意味着设备处于持续 RESET 状态。鉴于此,我将提出一些问题,以帮助进一步分析观察到的行为: 请问MCU的PTD0/RESET_b引脚是否连接了任何硬件/电路?它浮空吗? VDD_IO_D 轨电压测量结果是否正常?因为该电源域驱动复位系统上的电压。有关电源管理硬件建议,您可以参考AN14742 。 您能否测量 RESET_b 引脚的电阻?如果可以,请提供测量值。 当您从外部执行强制复位时,是否将外部电压直接连接到复位引脚? 请告知我所需信息。 Re: MCXW727CMFTBT — SWD connection fails on factory-blank devices (2 units, identical failure) 你好@Rwaka ,谢谢你提供的信息。 为了更好地分析观测到的测量结果,能否请您分享一下电路板的原理图? 此外,鉴于测得的电阻值较低,请尝试添加一个阻值在 10kΩ-100kΩ 之间的外部上拉电阻?正如以下社区帖子中所建议的:调试的设计考虑因素。 另外,能否请您提供一下在 RESET_b 引脚上观察到的 RESET 信号的示波器波形图? Re: MCXW727CMFTBT — SWD connection fails on factory-blank devices (2 units, identical failure) 你好@RomanVR , 感谢您的支持。以下是我们硬件配置的尺寸和详细信息: PTD0/RESET_b 上的电路: PTD0/RESET_b 引脚(引脚 23)直接连接到我们的 10 针 SWD 调试接头(FTSH-105)的引脚 10。该PCB网络上没有外部上拉电阻或去耦电容;它完全依赖于MCU的内部上拉电阻。 VDD_IO_D 轨电压:直接在引脚处测量到轨电压为3.28V ,这完全在 AN14742 规定的预期标称电压范围内。 RESET_b 引脚的电阻:在电路板未通电的情况下,我测量到 RESET 引脚对地电阻异常低,为 38 欧姆。 External RESET test: 我在 RESET 线上的 3.3V 处添加了一个外部 4.7 kΩ 上拉电阻,以测试它是否会将引脚拉高。然而,这样做并没有效果,SWD 连接仍然失败,这与 38 欧姆的接地阻抗完全压倒上拉电阻的情况相符。 鉴于我们两块出厂空白的 MCXW727CMFTBT 芯片都存在 38 欧姆近乎短路到地线的情况——而我们的 MCXW716C 芯片在相同的 PCB 布局上开箱即用——这是否表明该批次(批号 PF2R73.00)存在硅/制造缺陷,或者是否存在内部硬件状况导致该线路拉低? 顺祝商祺! Re: MCXW727CMFTBT — SWD connection fails on factory-blank devices (2 units, identical failure) 你好,又见面了。 后续所有测试均在我们第三台全新未使用过的设备(此前从未通电/触碰过)上进行: 外部上拉电阻(10 kΩ,在您要求的 10kΩ–100kΩ 范围内): RESET_b,未通电,接有 10 kΩ 上拉电阻: 16 kΩ (正常 - 与单独测量的内部 ~313 kΩ 一致,与我们的外部 10 kΩ 并联) RESET_b,电路板上电后,由于仍然使用相同的 10 kΩ 上拉电阻,电压立即降至0.013 V。 SWD 连接尝试(相同设置):仍然失败,错误信息相同——错误:检测到错误的 DM-AP IDCODE:0xFFFFFFFF 上电时 RESET_b (PTD0) 的示波器波形:并非如我们最初报告的那样是一条硬平线——仔细观察(1ms/div,500mV/div)显示了一个真实的瞬态过程:引脚上升到大约1V (而不是 3.3V),以轻微的上升斜坡保持该部分电平约1ms ,然后急剧下降并保持低电平。无论是否使用外部 10 kΩ 上拉电阻,都会出现相同的瞬态波形,并且通过直接探测 MCU 引脚(而不仅仅是调试连接器)证实了这一点——因此,这是引脚上的真实信号,而不是电缆/连接器产生的伪影。将时间基准扩大到 100 毫秒/格,然后再扩大到 1 秒/格,可以确认这是一个单一的、一次性的事件——没有重试,没有重复循环。这看起来像是 MCU 尝试释放 RESET_b 一次失败/部分尝试,然后永久停止,而不是重复的欠压/看门狗循环,或者引脚从一开始就被保持在 0V。 示波器在 OSC1 输出端(引脚 3,SIT8918BA 有源振荡器)上显示:确认存在且稳定的干净 32.000 MHz 方波——因此,主系统时钟到达 EXTAL 的原因可以排除。 补充数据点——官方 FRDM-MCXW72 板:使用完全相同的探针,我们成功连接并刷写了真正的 NXP FRDM-MCXW72 评估板,没有任何问题。该板上的 MCU 标记显示为:MCXW72 / 7CMFTB / 3P57K / S1953603 — 确认其零件编号 (MCXW727CMFTB) 和掩模组 (3P57K) 与我们故障的定制板单元相同,只是批号/日期代码不同 (S1953603 对比我们的 PF2R73.00)。这有力地证实了探头/电缆/工具没有问题,并指出问题出在 PF2R73.00 批次上,而不是零件号或掩模组本身。 摘要:上电前 RESET_b 电气性能良好(313 kΩ 隔离 / 16 kΩ 带外部上拉),32 MHz 振荡器运行正常,但上电后 RESET_b 电压瞬间降至接近 0V 并保持在该电压状态——即使施加 10 kΩ 外部上拉电阻——SWD 始终无法连接,即使按住复位键(r/h/connect)也是如此。这表明 MCU 本身在其启动序列的早期就主动将 RESET_b 拉低,并且从未释放它,而不是被动/外部电气问题。在完全未改动的设备上可重复,以一台工作正常的 FRDM-MCXW72(相同探头)作为阳性对照。 附上原理图摘录(RESET_b / SWD 接头网络、时钟部分)。 请告诉我们接下来什么最有帮助——我们很乐意在连接尝试期间尝试 SWDCLK/SWDIO 示波器捕获,或者进行任何其他测试。 顺祝商祺! Re: MCXW727CMFTBT — SWD connection fails on factory-blank devices (2 units, identical failure) @Rwaka你好,感谢你执行了所需的测试。 请问您能否分享一下您的集成电路的详细照片?包括您定制的电路板和二手的FRDM电路板。 此外,关于您的原理图,我建议您参考AN14802 - MCX W71 到 MCX W72 的迁移指南和AN14742 - MCX W72 的电源管理单元硬件,以确保电源配置正确(例如)。排除不支持的电源模式实现或电源配置错误),并缩小观察到的行为范围。 Re: MCXW727CMFTBT — SWD connection fails on factory-blank devices (2 units, identical failure) 你好, 对照我们的原理图检查了 AN14802/AN14742——在 IC 图片之前有一个问题。 DCDC_LX:在我们的电路板上悬空(没有外部电感器),与 AN14742 的“低成本”配置相匹配。但禁用 DC-DC 需要软件写入,而这在我们空白/从未编程的设备上永远不会发生——因此 DC-DC 保持其硬件默认启用状态,LX 处于浮空状态。不过,我们正常工作的 MCXW716C 电路板也采用了完全相同的布局。 这种(DC-DC启用,LX浮空)是否真的能阻止空白MCXW727C在任何代码运行之前启动/写入? 将 DCDC_LX 暂时连接到 GND 是否是一种安全的测试方法,还是应该避免这样做(内部开关节点,没有电感器/缓冲电路)? 附图为集成电路图片(定制板+FRDM板,芯片标记)。 顺祝商祺! Re: MCXW727CMFTBT — SWD connection fails on factory-blank devices (2 units, identical failure) 你好@Rwaka , 请问您在设计中采用了哪种电源配置方案? 前面的问题提供了重要的背景信息,因为如果您使用的是“低成本/旁路”供电配置,建议按照 AN14742 中所述将 DCDC_LX 引脚浮空;如果您没有实现此供电配置,则该引脚不能悬空。 关于这个主题,我建议参考MCXW72 数据手册中的表 58。表 58 为未使用的接口推荐连接,以确保根据您的电源配置,未使用的接口具有正确的引脚连接。 Re: MCXW727CMFTBT — SWD connection fails on factory-blank devices (2 units, identical failure) 你好@Rwaka ,感谢你对照共享文档进行核对。 能否提供一下VDD_CORE/VOUT_CORE引脚和VDD_LDO_CORE引脚的信号示波器测量结果? 此外,如果您无法分享完整的原理图,请参考以下社区帖子:使用 KW47(汽车)或 MCX W72(物联网/工业)首次正确构建 PCB 的最佳方法?文章末尾分享了以下两个文件: KW47 MCXW72 设计检查清单 V3.xlsx:用于确定设计是否完全符合 W72 的正确特性的检查清单。 KW45 - MCX W71 - KW47 - MCX W72 最低物料清单演示客户 5 月 26 日.pdf:针对您的配置(LDO 模式)推荐的外部组件和连接提供指导。 请对这两个指定的文件进行交叉核对,并将结果告知我。 Re: MCXW727CMFTBT — SWD connection fails on factory-blank devices (2 units, identical failure) 你好, 确认:我们的板采用“低成本/旁路”供电配置——没有外部 DC-DC 电感,DCDC_LX 浮空。 我们按照建议,对照表 58(数据表)进行了交叉核对。我们的布局符合那里关于直流-直流相关引脚的建议: DCDC_LX:浮空 ✓(符合“浮动”建议) VSS_DCDC:接地 ✓(符合“始终连接到 VSS”建议) 我们没有发现原理图这一部分存在任何差异。如果您希望我们专门重新检查表 58 中的其他引脚/区域,或者您有其他角度需要调查,请告诉我们。 顺祝商祺! Re: MCXW727CMFTBT — SWD connection fails on factory-blank devices (2 units, identical failure) 你好, 我们找到了——感谢您的指导! 根本原因:我们定制的电路板上的VOUT_SYS/VDD_SYS(引脚 22)根本没有去耦电容——完全悬空,没有任何连接。与您指出的官方 FRDM-MCXW72 原理图相比,该板使用 4.7µF + 1.5µF + 0.1µF 并联对该引脚进行去耦(R36/LDO_SYS_BYPASS 在那里也是 DNP,因此 VDD_SYS 完全是内部生成的,只是进行了深度去耦)。 我们在第三个(之前未改动过的)单元的 VDD_SYS 和 GND 之间添加了一个 4.7µF 的电容——SWD 立即连接,刷写功能也正常工作。 有趣的是,我们的 MCXW716C 板上也存在完全相同的浮动 VDD_SYS(完全没有电容),而且这些板工作正常——因此,这似乎是 W71 和 W72 电源管理单元之间真正的行为差异(可能与 AN14664 中提到的新的 DC-DC 斜坡控制功能有关,W71 没有此功能),而不是文档上的疏漏——表 58 确实将 VDD_SYS 列为“除了去耦电容外,其余部分为浮动”,但没有指定最小值,很容易忽略它在 W72 上有多么关键。 我们将在下一个板版本中为 VDD_SYS 添加适当的去耦(与您的参考值匹配),并且还将检查我们的另外两个单元(它们在之前的测试中还出现了与此无关的自致 RESET_b 异常)。 非常感谢您一直陪伴我们——表 58 / 最小物料清单交叉检查建议正是我们所需要的。非常感谢您的支持。 顺祝商祺! Re: MCXW727CMFTBT — SWD connection fails on factory-blank devices (2 units, identical failure) 你好@Rwaka ,希望你一切都好。 请您另开一个帖子,详细说明您的问题,以便我们能将您的问题转交给相应的团队并得到妥善解答。 这有助于我们更好地跟踪技术问题,并为客户提供更好的支持。 感谢您的理解。 Re: MCXW727CMFTBT — SWD connection fails on factory-blank devices (2 units, identical failure) 主题:推荐请求:MCX W71 与 MCX W72,适用于寿命超过 15 年的 CE 认证工业产品 尊敬的恩智浦团队: 我们正在开发一款工业产品(非接触式电源和数据连接器),采用专有的 2.4 GHz GenFSK 链路。我们的 PCB(48QFN)可与 MCX W71(MCXW716CMFTAT)和 MCX W72(MCXW727CMFTB,以 MCXW727CMFTBT 形式提供)配合使用。我们现在必须从中选择其中一个,并在获得 CE(RED)认证之前确定设计方案。我们产品的预期寿命超过 15 年,如果元器件停产或更换,我们无法承担重新认证的费用。 您能否告诉我们,对于这种使用场景,您推荐哪一款,以及原因?尤其: 1. 对于需要保持可用性超过 15 年的新设计,您推荐哪种设备?它们是否被定位为过时设备或不推荐用于新设计的设备? 2. 请以书面形式确认每款产品的当前生命周期状态、最短使用寿命(10 年或 15 年)、作为参考,引用的用上市,不用发布上市日期以及产品寿命计划中的“计划截止日期”。NXP 社区的回答中提到 W72 的停产日期为“至 2040 年”,但我们没有找到 W71 的已公布停产日期。 3. 由于我们的目标超过了标准的 15 年期限,能否延长任一设备的寿命(该计划的“延长”状态)?如果没有,对于使用寿命超过 15 年的产品(最后一次购买、停产前通知期、外形、功能和尺寸都合适的后续产品),您有什么建议? 4. 任何计划中的产品变更通知 (PCN)、产品终止通知 (NRND) 或产品生命周期结束通知 (EOL),以及计划中的迁移路径(如有)。 5. 任何计划中的掩模/硅修改或制造地点转移,都可能改变射频特性(输出功率、谐波、杂散发射)。这两个设备使用不同世代的无线电技术,因此我们认为我们的无线电测试报告无法在它们之间共享。是这样吗?你们是否有可以帮助我们测试实验室的射频特性数据? 如果能有一份正式的资历证明,并将其纳入我们的认证文件中,将会非常有帮助。 提前谢谢您。 顺祝商祺!
查看全文
EB tresos 用の MCP サーバー 私はelectrobitが提供するMCPサーバー、またはEB Tresos用に開発されたAPIを探しています。
查看全文
NXP S32M276CHABMKHSR VPRE output voltage range Hello,  I have a question about the VPRE output voltage range of NXP S32M276XX IC. I used external P-MOSFET voltage-regulator for VPRE in my design as below shows. Ted_Qiao_0-1788752795769.pngTed_Qiao_0-1788752795769.pngTed_Qiao_0-1788752795769.pngTed_Qiao_0-1788752795769.png When external P-MOSFET regulator is activated(set CONFIG-VPREEXT = 1), the output voltage of VPRE pin is around 7.0V; When external P-MOSFET regulator is not activated(set CONFIG-VPREEXT = 0, then internal regulator to be used), the output voltage of VPRE pin is around 6.3V. The status that I described is normal or not? What exactly output range is the VPRE in both status? By the way, In the datasheet, the typical output voltage of VPRE is 6.4V. Ted_Qiao_1-1788753322135.pngTed_Qiao_1-1788753322135.pngTed_Qiao_1-1788753322135.pngTed_Qiao_1-1788753322135.png Re: NXP S32M276CHABMKHSR VPRE output voltage range Hello @Ted_Qiao, The two regulators, one using the external ballast PMOS and the other using the internal ballast PMOS, are enabled by default. The external regulator has a slightly higher regulation point, so it is the only one active under normal conditions. The internal regulator becomes active only when the external regulator is disabled. The exact regulation points are not specified in the datasheet. Only a typical value of 6.4 V is provided for both the internal and external regulators. The actual regulation point depends on production variations and operating conditions. For example, on my EVB I measured approximately 6.2 V with the internal ballast PMOS and approximately 6.8 V with the external ballast PMOS. The absolute maximum rating for VPRE is 7.5 V, so the voltage you measured is well below this limit. BR, Daniel Re: NXP S32M276CHABMKHSR VPRE output voltage range Hi @Ted_Qiao, Between resets, these bits can only be changed once, from 1 to 0. As shown below, the reset value of both bits is 1, and they can only be written to 0. Therefore, if you need to change any of them back to 1, the MCU must be reset. danielmartynek_0-1788937659360.pngdanielmartynek_0-1788937659360.png danielmartynek_1-1788937747975.pngdanielmartynek_1-1788937747975.png Regards, Daniel Re: NXP S32M276CHABMKHSR VPRE output voltage range Hi Daniel, Thanks for your explanation. It's clear for me now. My further question, how could I switch freely between internal regulator mode and external regulator mode in application software? I try to set the relevant register according to [S32M27x Reference Manual], Set if using VPRE internal regulator (VPREINT=1, VPREEXT=0) or using VPRE external regulator (VPREINT=0, VPREEXT=1). But it could not switch freely during operating mode.  The background for doing it is that I want to do some tests with the regulator mode switching. Thanks!  Ted_Qiao_0-1788917986227.png
查看全文
HSE installation issues Help! I have written a routine for HSE firmware installation by referring to the official demo project. However, no data is present at the HSE installation address 0x007E0000 after I perform two resets. Does this mean the HSE installation has failed? 1131_0-1788746050565.png1131_0-1788746050565.png This is the ld file 1131_1-1788746137817.png1131_1-1788746137817.png This is the rewritten IVT vector 1131_2-1788746175542.png1131_2-1788746175542.png 1131_3-1788746225953.png1131_3-1788746225953.png 1131_4-1788746253844.png1131_4-1788746253844.png Finally, I attach my HSE installation demo project. Re: HSE installation issues The S32 version is 3.6.8, the chip is S32K314, and the RTD version is 7.0.1 Re: HSE installation issues At first you should see HSE_CONFIG_GPR3 register (0x4039C028) to find out whether your HSE FW is installed or not. 
查看全文
HSE安装问题 帮助!我参考官方演示项目编写了一个 HSE 固件安装程序。但是,在执行两次 RESET 后,HSE 安装地址 0x007E0000 处没有任何数据。这是否意味着 HSE 安装失败了? 1131_0-1788746050565.png1131_0-1788746050565.png 这是 ld 文件 1131_1-1788746137817.png1131_1-1788746137817.png 这是重写的 IVT 向量 1131_2-1788746175542.png1131_2-1788746175542.png 1131_3-1788746225953.png1131_3-1788746225953.png 1131_4-1788746253844.png1131_4-1788746253844.png 最后,我附上我的 HSE 安装演示项目。 Re: HSE installation issues S32 版本为 3.6.8,芯片型号为S32K314,RTD版本为7.0.1。 Re: HSE installation issues 首先,您应该查看 HSE_CONFIG_GPR3 寄存器 (0x4039C028),以确定您的 HSE 固件是否已安装。
查看全文
i.MX RT1176 – FlexIO2 parallel receive: maximum achievable shift clock? Only ~48 MSPS reached iMXR1176 SDK 25.09.00 Manifest 3.15.0 Goal I am acquiring data from an LTC2164 16-bit ADC on an i.MX RT1176. The data path is: LTC2164 (full-rate CMOS output) → FlexIO2 (parallel RX) → eDMA → external SDRAM Hardware setup LTC2164 configured in full-rate CMOS output mode, clocked by an external 100 MHz oscillator (so 100 MSPS, 16-bit parallel). ADC data outputs D0–D15 connected to GPIO_AD_00 … GPIO_AD_15. ADC CLKOUT+ connected to GPIO_AD_30, used as the FlexIO timer clock (external pin clock source). Software setup FlexIO2 configured as a parallel receiver, data latched into shifter 7; shifters 7->0 are chained so that 32 bytes are buffered before the DMA request is asserted. eDMA triggered by kDmaRequestMuxFlexIO2Request0Request1, using two TCDs in ping-pong (scatter/gather) mode. An interrupt is raised on each major loop completion, i.e. every 16384 samples. FlexIO2 functional clock: 120 MHz. Bus clock (eDMA / SEMC side): 240 MHz. Problem At 100 MSPS, 16384 samples should take 163.84 µs. Measuring the time between two consecutive DMA interrupts (GPIO toggle + scope), I consistently get 338 µs, i.e. a factor of ~2.06. This corresponds to an effective sustained rate of about 48 MSPS, which suggests the bottleneck is on the FlexIO side rather than the ADC or the SDRAM. Questions Is there a documented maximum shift clock frequency for FlexIO in parallel receive mode on the RT1176? I could not find any such figure in the RM or the datasheet. When the timer clock source is an external pin, what is the required ratio between the FlexIO functional clock and the external shift clock? My FlexIO clock (120 MHz) is only 1.2× the incoming 100 MHz clock — is that sufficient, or does the input synchronization logic require 2× or 4×? Given the almost exact ×2 ratio I observe, could this come from the FlexIO timer decrementing on both edges of the clock (TIMCMP convention), meaning my timer compare value effectively halves the throughput? Any guidance on the maximum realistic sustained throughput of FlexIO + eDMA on this part would be very helpful, since this determines whether I need to move to a different peripheral or an external FIFO. Thanks in advance. Communication & Control(I3C | I2C | SPI | FlexCAN | Ethernet | FlexIO) Re: i.MX RT1176 – FlexIO2 parallel receive: maximum achievable shift clock? Only ~48 MSPS reached Hello, thank you for your reply. I was indeed able to achieve the desired performance, but only by exceeding the maximum recommended clock frequency for the Flexio peripheral; specifically, instead of configuring the clock at 120 MHz, a clock speed greater than 200 MHz is required to achieve 100 MSps acquisition, whereas a 120 MHz configuration results in missed clock edges. The problem is that, even though it works at 200 MHz (despite the Reference Manual specifying a 120 MHz maximum), I have no guarantee of reliable operation under varying temperature conditions or across different production batches. Re: i.MX RT1176 – FlexIO2 parallel receive: maximum achievable shift clock? Only ~48 MSPS reached Hello @azed38,   Please keep in mind that when an external pin is used as the clock source, a small synchronization latency is introduced. According to Section 67.3.3.2 of the RM, this latency can range from 0.5 to 1.5 FlexIO clock cycles: Habib_MS_1-1788818202534.pngHabib_MS_1-1788818202534.pngHabib_MS_1-1788818202534.png Regarding the maximum throughput achievable with FlexIO and DMA, there is not a performance test for the FlexIO  and DMA. However, you may find the AN12686 useful, as it demonstrates a parallel communication implementation using FlexIO and DMA, this may provide guidance relevant to your use case. BR Habib Re: i.MX RT1176 – FlexIO2 parallel receive: maximum achievable shift clock? Only ~48 MSPS reached Hello @azed38, I noticed that you are already receiving support through another channel regarding this topic, so the support will continue there to keep all communication centralized. I would only like to add that operating FlexIO beyond its maximum frequency specifications could cause unexpected behaviors affecting your end application. Based on the information provided in Table 15-4 "Clock Roots" of the RM, I recommend using a maximum frequency of 120 MHz. BR Habib Re: i.MX RT1176 – FlexIO2 parallel receive: maximum achievable shift clock? Only ~48 MSPS reached Hi, The issue is likely due to the pin synchronization delays that are described on section "67.3.3.2 Pin Synchronization" of the Reference Manual. Considering the setup mentioned before, the root cause of the issue is the ratio between the incoming data frequency, and the operating clock frequency on the FlexIO, from the aforementioned pin synchronization delays of this module. For example, because of the pin synchronization delays that exists, the FlexIO emulated peripherals like SPI Master can only operate at a maximum baud rate of one fourth of the FlexIO operating clock frequency. As noted on the RM on section 67.4.3: "Due to synchronization delays, the setup time for the serial input data is 1.5 FlexIO clock cycles, so the maximum baud rate is divided by 4 of the FlexIO clock frequency." In this case, the throughput is expected to be decremented, and as the pin synchronization delays are an inherent behavior of the FlexIO module, there is no workaround. Because of this, combined with the maximum operating frequency of the FlexIO module of 120MHz to ensure proper operation, an expected 100MSPS will not be possible on the RT1170. BR Habib Re: i.MX RT1176 – FlexIO2 parallel receive: maximum achievable shift clock? Only ~48 MSPS reached > Given the almost exact ×2 ratio I observe, could this come from the FlexIO timer decrementing on both edges of the clock (TIMCMP convention), meaning my timer compare value effectively halves the throughput? Just wanted to mention that yes, FlexIO timers are dual-edge sensitive when clocked from a Pin or Trigger. So, if your external signal makes one rising and one falling edge, your timer will count twice towards its compare value.  Also, based on my general experience with FlexIO so far, I'd guess that you can only work with external signals up to half the FlexIO clock rate. How else could it sense dual edges? It has to sample the external pin twice per clock period in order to detect the edge.
查看全文