2396694_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2396694_en-US

2396694_en-US

mex config generate code different from windows and linux

The same XEM file generates different code on different systems.
Windows  file generate code normal but linux system generate abnormal
precondition:the same as RTD and SDK version install5.jpg

Re: mex config generate code different from windows and linux

Hi @Litten 

Currently, RTDs are supported only on the Windows platform and are not officially supported on Linux. Even if you are able to install them on Linux, you may encounter additional issues during development and integration.

One of the main reasons is that Linux is a case-sensitive operating system,  details about this situation have been discussed in the thread Problems with Lpi2c_Ip_MasterConfig and Lpi2c_Ip_SlaveState struct generation on S32DS for S32K344.


BR, VaneB

タグ(1)
評価なし
バージョン履歴
最終更新日:
3 週間前
更新者: