IW610G 802.15.4/SPI completely silent Hi, We're integrating an IW610G module (Murata TYPE2LL) on a custom embedded Linux board and need help getting 802.15.4/Thread working over SPI. WiFi and BLE work perfectly on the same hardware/firmware only the 802.15.4 RCP is an issue. Posting with as much detail as possible to save round-trips. Hardware/software setup - Host: QCA9531 SoC (MIPS 24Kc), OpenWrt-based Linux 6.12, ath79 target - IW610G (Murata TYPE2LL) connected via USB for WLAN and BLE, and SPI for 802.15.4 matching the standard IW610 host interface architecture - Firmware: usbusbspi_iw610.bin.se, pulled from the public nxp-imx/imx-firmware repo - otbr-agent/ot-daemon built with -DOT_POSIX_RCP_SPI_BUS=ON and related options, using its built-in spinel+spi:// transport (spidev-based, no custom kernel SPI driver we understand this matches NXP's intended architecture, since NXP doesn't ship an in-kernel driver for the SPI/802.15.4 side) What works - WiFi: full association, throughput and stability tests over USB, 5 GHz, confirmed with real traffic under sustained load - BLE: advertising, scanning, and coexistence with WiFi all confirmed working over USB with real nearby devices detected What doesn't work - 802.15.4 over SPI: the host correctly asserts CS, clocks out well-formed Spinel RESET frames, and the RCP never replies anything always a zero-filled header. This is consistent: - Across every SPI clock speed from the controller's hardware floor up to 20 MHz - With or without a GPIO reset pulse on IND_RST_WL/IND_RST_NB (chip-select/reset lines tested individually and combined) - Across multiple wake/reset GPIO (WL_WAKE_IN, NB_WAKE_IN) - On a chip confirmed freshly and cleanly power-sequenced What we've already ruled out on our side - Electrical signals confirmed clean and correctly timed scope-verified - SPI mode (CPOL=0/CPHA=0) and timing verified against the IW610 datasheet's own SPI host interface timing diagram - Firmware confirmed present, correctly loaded, and up to date (matches the latest commit on nxp-imx/imx-firmware) The FP92/FP99 discrepancy Our driver reports: wlan: version = USBIW610--18.99.8.p52--MM6X18543.p18-GPL-(FP92) We found an existing thread ("IW610 802.15.4 problems") where another user hit the exact same symptom with the exact same (FP92) tag, using sduartspi_iw610.bin.se. RN00104 documents USB-WLAN-USB-BLE-FP99-IW610 as the official validated configuration for IW610 over USB (WLAN over USB, BLE over USB matching our exact bus topology). Digging further: -The public nxp-imx/mwifiex repo has FPNUM="92" hardcoded in the Makefile on every branch we checked, including current HEAD - The public nxp-imx/mwifiex-iw612 repo does have a real FPNUM="99", but it's IW612-only (no IW610 references in the source) and SDIO-only (no USB transport code at all) Our question Where can we obtain the actual FP99 driver + firmware + config bundle corresponding to the USB-WLAN-USB-BLE-FP99-IW610 entry documented in RN00104 doc? Is this combination available through a channel other than the public GitHub repos (direct support request, NDA, module vendor distribution)? Any pointer to what's actually different between an FP92 and FP99 build beyond the version-string macro would also help us understand whether this is even the right lead. Thanks in advance Re: IW610G 802.15.4/SPI completely silent Hi,
I sent you a private message.
Regards, Daniel.
查看全文