Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
如何在停止并重新启动附件中的 CAN 分析仪后发送多个 CAN 消息 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> RHinnen 嗨, RHinnen 您能否抽出宝贵时间帮我解决以下问题:如何修改附件中的模型,使其能够发送多个 CAN 消息,并在 CAN 分析仪停止并重新启动后无需 RESET MCU 即可持续发送 CAN 消息?MPC574xP 示例项目-通信中提供的示例 -CAN1(Flexcan 交通)不存在此问题。 到目前为止,即使我在模型中添加了另一个 CAN 消息(不同的 ID),CAN 分析器也只发送了一个 ID 的 CAN 消息。CAN分析仪在停止和启动后将停止发送CAN消息。 期待您的解答,非常感谢! 示例模型 Re: How to send multiple CAN messages after stop and restart the CAN analyzer in the model attached 你好, 我也在寻找解决同样问题的方法。 如果您解决了无需重启MCU即可发送CAN信号的问题。请分享一下您的方法,这对我的项目很有帮助。 谢谢你, 拉胡尔 Re: How to send multiple CAN messages after stop and restart the CAN analyzer in the model attached <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好sparkee , 是的,很遗憾,如果您想使用同一个 MB 空间进行多次传输,您必须执行以下操作之一: - 要么使用阻塞模式(这可能会稍微降低应用程序的速度) - 可以使用非阻塞模式,但要确保在同一 MB 上进行的第二次传输只有在第一次传输完成后才会进行。否则,第一次转账会被第二次转账阻止,因此无法完成。 第二种选择取决于你如何编写应用程序,因为你必须自己管理时间——尽管如此,它的优势在于应用程序运行速度会稍快一些(取决于你通过时间管理增加的开销)。 第一种选择很简单(阻塞处理一切),但你必须决定在你的应用程序中,阻塞传输所花费的那一点额外时间是否是你能接受的。 最佳方案是拥有足够的可用空间(以 MB 为单位),以便可以使用非阻塞模式,每次传输都有自己的 MB 空间。 希望这样能解释清楚一些。 此致敬礼, 拉兹万。 Re: How to send multiple CAN messages after stop and restart the CAN analyzer in the model attached <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 这个问题是11月份提出的……现在有进展吗? 我发现的问题是,我没有为每条消息设置不同的消息缓冲区。我之前没意识到需要设置每条消息加载到特定的缓冲区中。 Re: How to send multiple CAN messages after stop and restart the CAN analyzer in the model attached <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 我仍然不知道正确的做法应该是什么。你能给我举个正确的例子吗? 谢谢。 Re: How to send multiple CAN messages after stop and restart the CAN analyzer in the model attached <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> paulvlase ‌, 请查阅并调查可能的解决方案。谢谢你! 丹尼尔
查看全文
Camera bring-up with imx95 Hi All, I am using the imx95 SVS setup imx95[SOC] + MX95MBDES01[MAX96724] ===> {mx95mbcam[0x03C10+MAX96717F]+mx95mbcam[0x03C10+MAX96717F]+mx95mbcam[0x03C10+MAX96717F]+custom_cam[0x03H10+MAX96717]} So basically, the entire setup is the same as SVS, but just changed the cam3 with a custom camera module [0x03H10+MAX96717]. I am making driver modifications but am facing an issue with the GMSL link lock. My custom camera module runs with this configuration: I2C Address: 0x84;Xtal Configuration Coax-Pixel Mode,6Gbps I can only see cam0-3: root@imx95-19x19-lpddr5-evk:~# i2cdetect -l i2c-1 i2c 44350000.i2c I2C adapter i2c-2 i2c 42530000.i2c I2C adapter i2c-3 i2c 42540000.i2c I2C adapter i2c-4 i2c 426b0000.i2c I2C adapter i2c-5 i2c 426c0000.i2c I2C adapter i2c-6 i2c 426d0000.i2c I2C adapter i2c-8 i2c i2c-2-mux (chan_id 0) I2C adapter i2c-9 i2c i2c-2-mux (chan_id 1) I2C adapter i2c-10 i2c i2c-2-mux (chan_id 2) I2C adapter Please suggest a solution. Re: Camera bring-up with imx95 so the orginal setup has 4 camera modules with MAX96724,right now you change one of the module cam3 with custom camera module MAX96717 and you can not find it. The module is chan_id 3,right? Re: Camera bring-up with imx95 Yes, that's correct Re: Camera bring-up with imx95 I got this fixed by running a correct SerDes config. Now, the camera is up, but getting too white video data. How can I do Image tunning? Attached a video for reference. Re: Camera bring-up with imx95 I got the image as output. How do I do image tuning: Attached the image and data which I have used. Re: Camera bring-up with imx95 First check: Is ISP actually being used? Run: libcamera-hello --list-cameras or media-ctl -p and verify the stream is going through: Sensor -> ISI -> ISP -> libcamera If you're bypassing the ISP and displaying RAW data directly, image quality will look very poor. The i.MX95 camera subsystem is designed to use the ISP for RAW Bayer sensors. Common cause #1: Wrong Bayer pattern You replaced the SVS sensor: OX03C10 with: OX03H10 One of the first things to verify is: BGGR RGGB GRBG GBRG If the Bayer order configured in the driver differs from the sensor output format, the image often appears: extremely bright wrong colors pink/magenta tint green tint Check the sensor mode table and DT endpoint configuration. Common cause #2: Exposure too high Try forcing exposure manually. For example: v4l2-ctl -d /dev/v4l-subdevX --all `` Check: exposure analog gain digital gain If exposure is fixed at a large value, the image will become completely white. Common cause #3: AE/AWB not working The i.MX95 ISP uses calibration/tuning information and IPA algorithms for: AE (Auto Exposure) AWB (Auto White Balance) Color correction Denoise Gamma The camera porting guide states that a sensor-specific configuration and calibration database must be created for a new sensor. If you simply copied the OX03C10 driver and changed the sensor ID, the ISP may still be loading OX03C10 tuning parameters, which are incorrect for OX03H10. Common cause #4: Wrong DTP / calibration database For i.MX95, tuning parameters are stored in sensor-specific database files: database_ _ _ _ .bin The porting guide states that a dedicated calibration file must be created for a new sensor and installed through the IPA configuration. Without proper calibration: exposure can be unstable white balance can be wrong colors can be inaccurate image may appear washed out Re: Camera bring-up with imx95 How to generate tuning bin files? Re: Camera bring-up with imx95 clear the camera without dust in the front; modify the background light and make the image more clean; modify the brightness and contrastness and check the result; modify the cable connect and make the joint robust btw, the MAX96717F and MAX96717 may have some parameter difference with serdes configuration
查看全文
S32K566 MCAL支持canxl吗?有demo吗 S32K566 MCAL支持canxl吗?有demo吗 Re: S32K566 MCAL支持canxl吗?有demo吗 Hi@leonchan2 你说的是在S32 DS中,在MCAL中选择CANXL组件吗? 如果是这样的话没有,我看到的是只可以在Driver中配置。 在EB Tresos的话,可以配置CANXL,并且我看到在S32 DS中我看到提供了一个工作在loop-back模式的demo。 S32K5的还没有mass market, 你可以联系你的代理商或者FAE来询问更多的细节问题。
查看全文
i.MX8M Plus - 使用 PCA9450C 时出现 WDOG_B# PU 错误 大家好, 使用 BSDL 模式是否需要在 WDOG_B# 引脚上安装 100k PU? 根据硬件设计指南,如果使用除 PCA9450 以外的 PMIC,则需要外部 PMIC。 可能需要上拉电阻(100 kΩ)来支持 边界扫描模式 在 EVK 设计中,100k PU 似乎安装在 WDOG_B# 引脚上,它们使用的是相同的 PCA9450 PMIC。 请确认。 PMIC Re: i.MX8M Plus - WDOG_B# PU when using PCA9450C 虽然 PCA9450C 默认禁用 WDOG_B 复位,并且正常操作并非严格需要上拉电阻,但 NXP 建议在需要边界扫描支持时添加 100 kΩ 上拉电阻。EVK 还安装了该电阻器,以确保在 BSDL 测试期间具有定义的 WDOG_B 电平,并避免在边界扫描模式下 WDOG_B 浮空时可能出现的RESET问题。
查看全文
添付モデル内のCANアナライザを停止・再起動した後に複数のCANメッセージを送信する方法 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ヒンネン こんにちは、 RHinnen 以下の問題を解決するために貴重な時間をいただけませんか?以下の問題を解消するために。CANアナライザーを停止・再開始した後もMCUをリセットせずに複数のCANメッセージを送信し続けるモデルを変更する方法について教えてください。MPC574xP サンプルプロジェクト - 通信で提供されているサンプル -CAN1 (Flexcan Traffic) には、この問題は存在しません。 これまで、モデルに別のCANメッセージ(異なるID)を追加しても、CANアナライザーはID CANメッセージを1つしか送っていません。CANアナライザは、停止および開始後にCANメッセージの送信を停止します。 解決策をお待ちしております。どうもありがとうございました! サンプル・モデル Re: How to send multiple CAN messages after stop and restart the CAN analyzer in the model attached こんにちは、 私も同じ問題の解決策を探しています。 もしその問題を解決したなら、MCUを再起動せずにCAN信号を送信してください。あなたのやり方を教えていただけると、私のプロジェクトに役立ちます。 ありがとう、 ラフル Re: How to send multiple CAN messages after stop and restart the CAN analyzer in the model attached <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、スパーク はい、残念ながら、同じMBを複数の転送に使用したい場合は、以下のいずれかの方法を取る必要があります。 - ブロックモードを使うか(アプリケーションの動作が少し遅くなる可能性が高い) - ノンブロッキングモードを使用するが、同じMB上での2回目の転送は、1回目の転送が完了した後にのみ実行されるようにする。そうでなければ、最初の転送は2番目の転送によって停止され、完了まで実行されません。 2つ目の選択肢は、**アプリケーション**の書き方によります。タイミング**マネジメント**は自分で行う必要がありますが、タイミング**マネジメント**のオーバーヘッドによっては、やや速い**アプリケーション**ができるという利点もあります。 最初の選択肢は比較的簡単です(ブロックがすべて処理します)が、その少しの余分な時間がアプリケーションに記載できるかどうかを決める必要があります。 最良のシナリオは、マネジメントが使えてノンブロッキングモードを使える場合で、転送ごとに専用のマザーボードセットが割り当てられている場合です。 これで少しは状況が明確になったでしょうか。 敬具 ラズバン。 Re: How to send multiple CAN messages after stop and restart the CAN analyzer in the model attached <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> この質問は11月に寄せられたものですが、何か進展はありましたか? 私が発見した問題点は、メッセージバッファをメッセージごとに個別に設定していなかったことでした。各メッセージを特定のバッファに読み込むように設定する必要があるとは知りませんでした。 Re: How to send multiple CAN messages after stop and restart the CAN analyzer in the model attached <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 正しいアプローチがどのようなものなのか、私にはまだ分かりません。正しい例を教えてもらえますか? ありがとう。 Re: How to send multiple CAN messages after stop and restart the CAN analyzer in the model attached <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ポールヴラーゼ、 ご確認いただき、解決策をご検討ください。ありがとう! ダニエル
查看全文
SJA1110 Qbv AdminBaseTime Configuration Dear NXP members, I have been working on the configuration of the SJA1110 switch on the S32G-VNP-RDB3 board for enabling the TSN features such as PTP and Qbv. I am using the SJA1110 SDK for S32 Design Studio to configure the switch, generate an updated sja1110_uc.bin file, and deploying it on the S32G board. Although I have been able to understand and test the configuration of most Qbv parameters, I was not able to grasp the correct configuration of the ADMINBASETIME[31:0] and ADMINBASETIME[63:32] on the QBV Administrative Parameters table. Screenshot 2026-07-01 094943.png According to the documentation in the document um549820-UM11107 Software User Manual for SJA1110(2.0), ADMINBASETIME is explained as: Defines the administrative value used for the base time, expressed in PTP/free running timescale, used for reference when calculating the moment in time when the reconfigured gate cycle begins (CycleStartTime) . But it does not provide any clue about how to calculate this value in a real project. Besides, the SJA1110 Qbv example on the SJA1110 Extended Configuration presentation uses 0 (start directly for this parameter). Let's imagine one example. Qbv is configured for the port 3 of the SJA1110 switch, which has a speed of 1000Mbps, and a granularity of 200 ns. One cycle has 500 μs and three segments: In the first segment, all Traffic Classes are open, except TC7. It lasts for 100 μs (TRIGGER_TIME = 500); In the second segment, only Traffic Class 7 is open, the other TCs are closed. It lasts for 300 μs (TRIGGER_TIME = 1500); In the third segment, all Traffic Classes are open, except TC7. It lasts for 100 μs (TRIGGER_TIME = 500). But in the same network there are another TSN switches configured with a Qbv cycle of 500 μs, but different segment intervals. How do I calculate ADMINBASETIME in order to synchronize between TSN switches and make sure it aligns with the gPTP time epoch? Thank you very much for your support! Re: SJA1110 Qbv AdminBaseTime Configuration Hello @GuilhermeS32G , Yes, ADMINBASETIME configuration ideally should be set programmatically during runtime to ensure that the Qbv on all switches is synchronized.  I would suggest to build the SJA1110 static configuration with ADMINBASETIME = 0. ADMINBASETIME should be programmed dynamically at runtime after gPTP synchronization is established. In that case, a host application, TSN management stack, CNC or other custom configuration software would read the current synchronized time, select a future base time with sufficient margin, write the Qbv administrative parameters (via dynamic reconfiguration) and trigger the configuration change. I would not recommend resetting the gPTP time at each startup only to make a fixed ADMINBASETIME valid. Best regards, Pavel Re: SJA1110 Qbv AdminBaseTime Configuration Hello @PavelL , Thanks for your support once again. So, from my understanding, this ADMINBASETIME configuration ideally should be set programmatically during runtime so to ensure that the Qbv schedule is in the future. In my case, as the SJA1110 switch is booting in SDL Boot, I am using the SJA1110 SDK for S32DS for programming its firmware. In this case, I would have to set the ADMINBASETIME in the QBV Administrative Parameters table; then build the new firmware file; deploy it into the S32G-VNP-RDB3 board; reboot the board so that the new configuration takes effect. The first time the ADMINBASETIME would be in the future, but then if I don't update the firmware in the subsequent runs, it would always have to adjust the active start time, as you have mentioned. In this case, wouldn't be better to simply set the ADMINBASETIME to 0? Otherwise, it would be better to reset the gPTP time during every start-up. Best regards, Guilherme Re: SJA1110 Qbv AdminBaseTime Configuration Hello @GuilhermeS32G , ADMINBASETIME should be understood as the absolute time reference/phase reference for the Qbv schedule. It is used to align the start of the repeating Qbv cycle to the synchronized time domain. It is not calculated from the port speed and it is not based on the TRIGGER_TIME granularity. In a multi-switch TSN system, gPTP / IEEE 802.1AS provides the common synchronized time base, but it does not automatically configure the Qbv schedule. The Qbv configuration, including ADMINBASETIME, must be programmed by a TSN management stack/CNC or by application-specific/custom software running on the host processor. IEEE 802.1Qcc describes centralized TSN configuration models where a CNC computes and distributes TSN configuration to the network devices.  https://www.ieee802.org/1/files/public/docs2017/cc-Kehrer-StartOfCycleReference-0117-v01.pdf A typical procedure might look like: 1. Start gPTP / 802.1AS and wait until all relevant TSN devices are synchronized. 2. Read the current synchronized time from the device/PTP time domain. 3. Choose a future base time: ADMINBASETIME = current_gPTP_time + safety_margin The safety margin should be large enough to allow the configuration to be written to all switches/ports before the selected base time is reached. 4. Program the same ADMINBASETIME and the same cycle time on all switches/ports that must share the same Qbv cycle phase. 5. Program the per-port GCL entries according to the required schedule. If alignment to the gPTP time epoch is required, the selected base time can also be aligned to the cycle boundary, e.g.: ADMINBASETIME = ceil((current_gPTP_time + safety_margin) / cycle_time) * cycle_time This is the same general idea used by Linux taprio: base-time defines when the schedule starts; if the base time is already in the past, the active start time is derived by adding an integer number of cycle times until the resulting start time is in the future. https://www.cisco.com/c/en/us/td/docs/switches/lan/cisco_ie4000/tsn/b_tsn_ios_support/b_tsn_ios_support_chapter_01.html https://deepwiki.com/nxp-qoriq/tsntool/5.2-device-configuration For SJA1110, the final ADMINBASETIME value must be encoded according to the time format expected by the SJA1110 Qbv configuration, and then split into: ADMINBASETIME[31:0] = lower 32 bits ADMINBASETIME[63:32] = upper 32 bits So, in summary: gPTP provides the common time; another software/configuration layer must choose and program the Qbv ADMINBASETIME relative to that time. This may be done by a TSN management stack/CNC or by custom application code in a simpler embedded system. Best regards, Pavel
查看全文
S32N55 HSE2 CRSドメイン認証が完了しません こんにちは、 私たちはS32N55上でHSE2ベースのSecure Debugを実装しており、SDC-600のデバッグ認証フロー(チャレンジ/レスポンス、APPモード、AES-256-CMAC)を用いています。これは、T32 CMMホストスクリプトがデバッグポートを介してSDC-600と通信して駆動されます。 **状態** - **FSSドメイン**:セキュアデバッグ認証が正常に完了します。デバッグターゲット `0x1A` (FSS) は、チャレンジ/レスポンスの交換後に `AUTHSTATUS = 0xBBB` を返し、ドメインのロックが解除されたことを確認します。 - **CRSドメイン**:認証が完了しない。CRSにはデバッグターゲット「0x1B」を使用しています(HSE2 FWリファレンスマニュアルからの確認待ち、下記質問1参照)。 **CRSの観測された挙動** 1. SDC-600 COMM_STARTとSoC Infoの交換が正常に完了しました。 2. ターゲット `0x1B` への AUTH_MODE_REQ は、予想どおり `AUTH_MODE = 0x0` (チャレンジベース) を返します。 3. APP_CHALLENGEリクエストが完了します;32バイトのチャレンジがFWから受信されます。 4. ADKPを使ってAES-256-CMACとしてチャレンジを計算し、16バイトの「appChallengeAuth」応答を送信します。この送信は、トランスポートレベルのエラーなく完了しました。 5. **この時点では、FWは`RxRESULT`を送信しません。**ホストスクリプトは、`rx_response_from_fw` での応答を待って停止します。`0xF2` (失敗) も ACK パターンもなく、応答がまったくありません。これは正常な障害とは異なります。ファイアウォールがこの要求に対する応答を生成する段階にすら達していないようです。 **現在の仮説** FSS側では、OTPのADKPを所有者の認可/認証キー(「HSE_SRV_ID_DEBUG_KEY_MAPPING」)として登録するために「Sherpa_Cdd_SetOwnerDebugKeyMap()」を一度呼び出します。このマッピングは、通話が発信されるMUチャネルの文脈でのみ適用されており、CRS側のHSE2インスタンスには見えないと推測されます。これが、CRSがストールするために明示的な失敗を返さずにCARD_REQUESTする理由を説明しています。 **質問** 1. `AUTH_MODE_REQ`と`CARD_REQUEST`におけるCRSドメインの正しいデバッグターゲット/ドメインID値は何ですか?現在、`0x1B`と想定していますが、確認または修正をお願いします。 2. `Sherpa_Cdd_SetOwnerDebugKeyMap()` (`HSE_SRV_ID_DEBUG_KEY_MAPPING`) はドメインごと/MUごとに発行する必要がありますか、それとも FSS と CRS で共有される単一のグローバルマッピングがありますか?ドメインごとに設定する場合、このサービスにおける対象となるMU/所有者はどのように選択されるのですか? 3. `SetOwnerDebugKeyMap` は起動のたびに呼び出す必要がありますか、それともマッピングは一度設定されると永続的になりますか (例:OTP/NVMの状態に紐づいているので、一度だけ呼び出せばいいのですか? 4. 'CARD_REQUEST'におけるCRSドメインに対して期待されるOID値は?現在、FSSで有効な方法と同様に、すべて`0xFF`(16バイト)を送信しています。 5. CRSドメインにおける`CARD_REQUEST`パケットの構造(`hseDebugCardCmd_t`)はどのようなものですか?`KRI`、`OID`、`AuthScheme`、またはデバッグドメインシグナルマップフィールドにおいて、FSS/APPドメインのレイアウトと違いはありますか? 6.CRSの「CARD_REQUEST」の認証タグはどのように計算すべきでしょうか?FSSと同じ「debugCardInfo」フィールド上でCMACで処理されるのか、それともCRSは異なるフィールドを含める必要がありますか? CRSドメインの想定されるシーケンス/値に関する情報があれば大変助かります。必要であれば、弊社のCMMスクリプトと取得したSDC-600バイトログを共有いたします。 よろしくお願いします。 Re: S32N55 HSE2 CRS domain authentication does not complete こんにちは、 @EddiePark 投稿ありがとうございます。 ご提示いただいた9つの質問につきましては、社内チームと協議を開始しており、現在も調査中です。進展があり次第、速やかにご回答いたします。 新たに挙げられた質問については、まず以前の質問と照らし合わせて確認し、その後一つずつ調査を進めていきます。 BR チェイン
查看全文
S32K566 MCALはCANXLをサポートしていますか?デモはありますか? S32K566 MCALはCANXLをサポートしていますか?デモはありますか? Re: S32K566 MCAL支持canxl吗?有demo吗 こんにちは、@ leonchan2 S32 DS内のMCALでCANXLコンポーネントを選択することについて言及されていますか? もしそうなら、いいえ、私が確認した限りでは、それはドライバーでのみ設定可能です。 EB TresosではCANXLの設定が可能で、S32 DSで提供されているループバックモードで動作するデモを確認しました。 S32K5はまだ量産市場に出回っていません。詳細については、販売店またはFAEにお問い合わせください。
查看全文
S32G3プラットフォームソフトウェア統合を用いてS32G3上でマルチコアアプリケーションを有効化する こんにちは; 私たちは、S32G399a に適用されたドキュメント AN13750 の手順を再現しようとしていますが、IPCF モジュールのビルドに関して懸念があります。 ドキュメントには「 0001-ipc-multi-instances.patch 」を使用するように記載されています。しかし、これはS32G3には適用されません。 TrikiIkram_0-1782919427268.png S32G3の場合、ドキュメントのすべての手順を進めてデュアルブートに成功するために、IPCFモジュールのビルドをどのように進めればよいか説明する方法はありますか? Re: Enabling Multicore Application on S32G3 using S32G3 Platform Software Integration こんにちは、 @TrikiIkram 投稿ありがとうございます。 1. S32G3に関するAN13750と同様の参考資料となるような公開文書がまだ存在しないことをお詫び申し上げます。 2. 現時点では、S32G3での使用方法のステップバイステップガイドではなく、AN13750を参考として使うことをおすすめします。S32G3プラットフォーム上でIPCFを設定する際は、マルチインスタンスサンプルではなく単一インスタンスサンプルを直接試すことをおすすめします。そうすれば、前述のパッチを適用する必要がなくなります。 BR チェイン
查看全文
RT1170 EVKB 双核示例:CM7 启动时卡住 大家好, 我刚开始使用RT1170 EVKB开发板,正在尝试运行位于以下位置的多核Hello World示例: boards/evkbmimxrt1170/multicore_examples/hello_world 我使用的是 MCUXpresso SDK v26.03.00(最新可用版本)。 当我加载多核示例时,CM7 内核在启动期间挂起,而调试器显示 CM4 内核正在运行。CM7 永远不会执行到 `main()`。 故障状态寄存器包括: cm7_hang.png 为了排除多核示例的问题,我还尝试运行独立的 CM7 Hello World 示例,但它表现出相同的行为。但是,独立的 CM4 Hello World 示例可以正常运行。 该电路板为RT1170 EVKB ,采用默认跳线和拨码开关设置,我没有修改任何硬件配置。 有人在使用 SDK 26.03.00或 RT1170 EVKB 时遇到过这个问题吗?CM7 内核是否需要任何额外的电路板配置、启动设置或调试器配置? 我还测试了之前的 SDK 版本( v2.13.0 ),但发现 CM7 内核也存在同样的问题。 任何建议都将不胜感激。 谢谢! Re: RT1170 EVKB Dual-Core Example: CM7 Hangs at Startup 嗨@FranklinOmo , 请问您能否分享一下您电路板的原理图版本?另外,为了简化审核流程,您能否给我们发送一张电路板的照片? 此致, 巴勃罗 Re: RT1170 EVKB Dual-Core Example: CM7 Hangs at Startup 嗨@Pablo_Ramos 以下是板的图片,供您参考。 IMG_6141.jpg Re: RT1170 EVKB Dual-Core Example: CM7 Hangs at Startup 嗨@FranklinOmo , 谢谢你提供的电路板照片。 你能帮我批量擦除板吗? 您可以在以下文档中找到使用 SPT 执行批量擦除的步骤: RT 开发板调试器连接问题恢复 您能否也帮我更新一下固件进行测试? 有关固件更新的说明,请参阅 MIMXRT1170-EVKB 板硬件用户指南第 2.11 节“板载调试器”。 您之前是否成功编程并运行过 CM7 应用程序?还是说,自从电路板从包装盒里拿出来后,就一直存在这种问题? 如果问题仍然存在,您能否尝试使用 GUI Flash Tool 或 SPT 对设备进行编程? 顺祝商祺! 巴勃罗
查看全文
SoC: i.MX8QXP (S1MX8QX5AVLF1BBと表記) 1782943205602.jpg 1782943232375.jpg 1782943282813.jpg 1782943341586.jpg 1782943372890.jpg Re: SoC: i.MX8QXP (marked S1MX8QX5AVLF1BB)brick こんにちは、 @Potesz さん ご質問は何ですか?問題について、より詳しい情報を提供してください。 BR
查看全文
LPC845 の GPIO への DMA 書き込みが失敗します LPC845 DMAはGPIOを0xA0000000で書き込めないようです GPIO書き込みを実行しようとすると、DMA0 ->ERRINT=1 というエラーが発生します。 トラブルシューティングの手順として、宛先アドレスをRAMに変更したところ、ERRINTフラグは発生しなくなりました。 これが本当に不可能なのかどうかを断定できる情報源は見つかりませんでした。 決定的ではないものの、その可能性を示唆する参考文献を見つけました: https://community.nxp.com/t5/LPC-Microcontrollers/Lpc-824-DMA-to-GPIO/m-p/650903 どなたか確認してもらえますか? Re: LPC845 DMA write to GPIO fails こんにちは、 @phatpaul ご質問ありがとうございます。 はい、LPC845 DMAコントローラはアドレス0xA0000000のGPIOレジスタ空間に直接書き込みできません。The GPIO ペリフェラル is コネクテッド through the Cortex-M0+ I/O bus for fast CPU アクセス, whereas the DMA コントローラ アクセス memories and supported ペリフェラル through the AHB/APB bus インフラ. さらに、LPC845のデータシートには次のように記載されています。 「DMAコントローラーはすべてのメモリとUSART、SPI、I2C、DAC、そしてキャパシティブタッチにアクセスできます。」 GPIOはDMAがアクセス可能なペリフェラルには含まれていません。したがって、GPIOレジスタ空間へのDMA転送はサポートされておらず、転送エラー(ERRINT)が発生します。これは、お客様が観察された動作と一致しています。 Alice_Yang_0-1783237995511.png よろしくお願いします。 BR アリス
查看全文
RT1170 EVKBデュアルコアの例:CM7が起動時にハングアップする こんにちは、皆さん 私は最近RT1170 EVKBボードを使い始めたばかりで、以下の場所にあるマルチコアHello Worldサンプルを実行しようとしています。 boards/evkbmimxrt1170/multicore_examples/hello_world 私はMCUXpresso SDK v26.03.00(最新バージョン)を使っています。 マルチコアのサンプルをロードすると、CM7コアが起動中にハングアップする一方、デバッガーではCM4コアが動作していることが示されます。CM7は`main()`に到達しません。 障害状態レジスタは以下のとおりです。 cm7_hang.png マルチコアの例に問題がある可能性を排除するため、スタンドアロンのCM7 Hello Worldの例も実行してみましたが、同じ動作を示しました。しかし、スタンドアロンのCM4 Hello Worldサンプルは正しく動作します。 ボードは RT1170 EVKB ( ジャンパーとディップ・スイッチ設定 )で、ハードウェア構成は変更していません。 SDK 26.03.00 やRT1170 EVKBでこの問題に遭遇した方はいらっしゃいますか?CM7コアを使用するには、追加のボード設定、ブート設定、またはデバッガー設定が必要ですか? 以前のSDKバージョン(v2.13.0)もテストしましたが、CM7コアでも同じ問題が起きていました。 何かご提案があれば大変ありがたいです。 ご回答をお待ちしています。 Re: RT1170 EVKB Dual-Core Example: CM7 Hangs at Startup こんにちは、@FranklinOmo さん。 基板の回路図の改訂版を教えていただけますか?さらに、レビューを簡素化するために、ボードの写真を送ってもらえますか? よろしくお願いします、 パブロ Re: RT1170 EVKB Dual-Core Example: CM7 Hangs at Startup こんにちは、 @Pablo_Ramos さん。 参考までに、ボードの画像を掲載します。 IMG_6141.jpg Re: RT1170 EVKB Dual-Core Example: CM7 Hangs at Startup こんにちは、@FranklinOmo さん。 ボードの写真をありがとうございます。 ボードの大量消去を手伝ってもらえますか? SPTを使ったマス消去の手順は以下の文書で確認できます: デバッガ接続の問題に対するRTボードのリカバリ ファームウェアのアップデートも手伝っていただけますか? ファームウェアの更新手順は、MIMXRT1170-EVKBボードハードウェアユーザーガイドのセクション2.11「搭載デバッガ」に記載されています。 これまでにCM7アプリケーションを成功裏にプログラム・実行できたことはありますか?それとも、この動作はボードを箱から出した当初からありましたか? 問題が続く場合は、GUI Flash ToolやSPTを使ってデバイスのプログラミングも試してみてはどうでしょうか? よろしくお願いいたします。 パブロ
查看全文
LS1028ARDb Yocto-SDKビルドの問題 こんにちは、 私はここに書かれている指示に従おうとしています。 https://github.com/nxp-qoriq/yocto-sdk LS1028ARDBのOSおよびSDKイメージを構築するために walnascarがデフォルトブランチのようですが、上記のリンク先の指示に従うとビルドが失敗します。 MKDIR Yocto-SDK CD YOCTO-SDK Repo init -u https://github.com/nxp-qoriq/yocto-sdk-b ワルナスカー リポジトリ同期 --強制同期 。./setup-env -m ls1028ardb bitbake fsl-image-networking これは3つのエラーで失敗します: - sysvinitインストールエラー - DTCネイティブコンパイルエラー - util-linux-native コンパイルエラー このドキュメントの手順も試してみましたが、誤った手順を回避したとしても、別の方法で失敗します(指定された「ls-image-desktop」が存在しません)。 https://docs.nxp.com/bundle/UG10081_LLDP_L6.1.55_2.2.0/page/topics/how_to_download_flexbuild.html flexbuildオプションも見つけ、ここに記載されている手順に従いました。 https://github.com/nxp/flexbuild git clone https://github.com/NXP/flexbuild.git CDフレックスビルド make docker ls1028ardb_defconfig を作成します すべてを作る これも以下のエラーで失敗します。 W: binfmt_misc が /proc/mounts に見つかりません -- マウントされていません OSイメージやSDKを構築する際の正しい手順は何ですか? よろしくお願いします。 マット Re: ls1028ardb yocto-sdk build problems 以下の最新のYocto Linux SDKリリースを使用してください。 今回のリリースには、以下に示すソースコードとビルド済みイメージの両方が含まれています。 ソースリリースファイルは、 https://github.com/nxp-qoriq/yocto-sdk/tree/walnascar-lsdkにあります。 ブランチ: walnascar-lsdk Linux BSP対応の基板、機能、既知の問題については、リリースノートをご参照ください Yocto用レイヤースケープソフトウェア開発キットユーザーガイド: UG10374.pdf Layerscape Linux SDK ユーザーガイド: UG10381.pdf 以下のプリコンパイル済みイメージは、 https://www.nxp.com/lgfiles/llsdk/walnascar/ にホストされています。 件 名称 説明 1 boot_ls1028ardb_lts_6.12.tgz LS1028ARDBのブートパーティションイメージ 2 boot_ls1043ardb_lts_6.12.tgz LS1043ARDBのブートパーティションイメージ 3 boot_ls1046ardb_lts_6.12.tgz LS1046ARDBのブートパーティションイメージ 4 boot_lx2160ardb-rev2_lts_6.12.tgz LX2160ARDBのブートパーティションイメージ 5 firmware_ls1028ardb_uboot_emmcboot.img LS1028ARDB eMMCブート用のBSPファームウェアイメージ 6 firmware_ls1028ardb_uboot_sdboot.img LS1028ARDB SDブート用BSPファームウェアイメージ 7 firmware_ls1028ardb_uboot_xspiboot.img LS1028ARDB XSPIブート用のBSPファームウェアイメージ 8 firmware_ls1043ardb_uboot_nandboot.img LS1043ARDB NANDブート用のBSPファームウェアイメージ 9 firmware_ls1043ardb_uboot_norboot.img LS1043ARDB NORブート用BSPファームウェアイメージ 10 firmware_ls1043ardb_uboot_sdboot.img LS1043ARDB SDブート用BSPファームウェアイメージ 11 firmware_ls1046ardb_uboot_emmcboot.img LS1046ARDB eMMCブート用のBSPファームウェアイメージ 12 firmware_ls1046ardb_uboot_qspiboot.img LS1046ARDB QSPIブート用のBSPファームウェアイメージ 13 firmware_ls1046ardb_uboot_sdboot.img LS1046ARDB SDブート用BSPファームウェアイメージ 14 firmware_lx2160ardb-rev2_uboot_emmcboot.img LX2160ARDB eMMCブート用BSPファームウェアイメージ 15 firmware_lx2160ardb-rev2_uboot_sdboot.img LX2160ARDB SDブート用BSPファームウェアイメージ 16 firmware_lx2160ardb-rev2_uboot_xspiboot.img LX160ARDB xSPIブート用BSPファームウェアイメージ 17 fsl-image-networking-ls1028ardb.rootfs.tar.gz Layerscape rootfsは基本的なネットワーク機能をサポートしていますLS1028ARDB 18 fsl-image-networking-full-ls1028ardb.rootfs.tar.gz Layerscape rootfsはLS1028ARDB上で完全なネットワーク機能をサポートしています 19 fsl-image-networking-ls1043ardb.rootfs.tar.gz Layerscape rootfsは基本的なネットワーク機能をサポートしていますLS1043ARDB 20 fsl-image-networking-full-ls1043ardb.rootfs.tar.gz Layerscape rootfsはLS1043ARDB上で完全なネットワーク機能をサポートしています 21 fsl-image-networking-ls1046ardb.rootfs.tar.gz Layerscape rootfsは基本的なネットワーク機能をサポートしていますLS1046ARDB 22 fsl-image-networking-full-ls1046ardb.rootfs.tar.gz Layerscape rootfsはLS1046ARDB上で完全なネットワーク機能をサポートしています 23 fsl-image-networking-lx2160ardb-rev2.rootfs.tar.gz Layerscape rootfsは基本的なネットワーク機能をサポートしていますLX2160ARDB 24 fsl-image-networking-full-lx2160ardbrev2.rootfs.tar.gz Layerscape rootfsはLX2160ARDB上で完全なネットワーク機能をサポートしています 25 フレックスインストーラー ツールの展開 画像展開の詳細はユーザーガイドの文書をご参照ください。 Debian Flexbuilder Linux SDKを使ってDebian Linux OSを使うこともできます。 Re: ls1028ardb yocto-sdk build problems この投稿の後、Flexbuild readme.md に載っていない前提条件がいくつかあるDebian Linux SDKユーザーガイドを発見しました。これにより、LS1028ARDB用のDebianベースのイメージを生成できるようです。 Yocto環境に似た方法でSDKを生成する手順は何ですか?それとも、標準的なクロスコンパイラをお勧めしますか? Debianソリューションは今やこのプラットフォームの推奨OSなのでしょうか?Yoctoは組み込みシステムにより適しているように感じます。 よろしくお願いします。 マット Re: ls1028ardb yocto-sdk build problems こんにちは、 ご意見ありがとうございます。しかし、walnascar-lsdk ブランチは、上記で説明した walnascar ブランチと同様のエラーで失敗します。 これは以下の出力です bitbake -k fsl-image-networking-full 概要:4つのタスクが失敗しました。 ~/walnascar-lsdk/sources/poky/meta/recipes-core/sysvinit/sysvinit-inittab_2.88dsf.bb:do_install log: ~/walnascar-lsdk/build_ls1028ardb/tmp/work/ls1028ardb-FSL-Linux/sysvinit-Inittab/2.88dsf/temp/log.do_install.1267212 Virtual:native:~/Walnascar-LSDK/Sources/Poky/Meta/Recipes-Core/Util-Linux/Util-linux_2.40.4.bb:do_compile log: ~/walnascar-lsdk/build_ls1028ardb/tmp/work/x86_64-linux/util-linux-native/2.40.4/temp/log.do_compile.1304034 virtual:native:~/walnascar-lsdk/sources/poky/meta/recipes-kernel/DTC/dtc_1.7.2.bb:do_compile log: ~/walnascar-lsdk/build_ls1028ardb/tmp/work/x86_64-linux/dtc-native/1.7.2/temp/log.do_compile.1321834 ~/walnascar-lsdk/sources/poky/meta/recipes-devtools/flex/flex_2.6.4.bb:do_compile log: ~/walnascar-lsdk/build_ls1028ardb/tmp/work/aarch64-FSL-Linux/Flex/2.6.4/temp/log.do_compile.2409352 概要:警告メッセージが17件ありました。 概要:6件のエラーメッセージが発生し、ゼロ以外の終了コードが返されました。 よろしくお願いいたします マット Re: ls1028ardb yocto-sdk build problems こんにちは、 返信ありがとうございます。結局、私のミスで、Ubuntuのバージョンを間違えていて、Yocto出力の警告を無視してしまいました。 24.04の開発コンテナに切り替え、以下の指示に従っています: Yocto: 用レイヤースケープソフトウェア開発キットユーザーガイドUG10374.pdf ビルドを実行したところ、問題なく動作しました。 よろしくお願いします。 マット Re: ls1028ardb yocto-sdk build problems ホストパッケージは以下の方法でインストールしてください。 sudo apt-get install build-essential chrpath cpio debianutils diffstat file gawk gcc git iputils-ping libacl1 liblz4-tool locales python3 python3-git python3- jinja2 python3-pexpect python3-pip python3-subunit socat texinfo unzip wget xzutils zstd efitools 問題が解決しない場合は、ログファイル ~/walnascar-lsdk/build_ls1028ardb/tmp/work/ls1028ardb-fsl-linux/sysvinit-inittab/2.88dsf/temp/log.do_install.1267212 を私に送って調査を依頼してください。
查看全文
S32セーフティソフトウェアフレームワーク(SAF)およびセーフティ周辺ドライバ(SPD)に関する質問 1. 安全周辺ドライバはリアルタイム・ドライバを*置き換える*のか、それとも補強するのか? 2. これらの両方(またはどちらか一方、あるいはどちらも)はソースコード形式で提供されていますか? 3. ソースコードが出荷用ファームウェアに含まれる場合、単位あたりのロイヤリティは発生しますか? 4. 開発キットごと/ユーザーごと/参照あたりのライセンスは、他の方法でカウントされるのか、それとも一度購入すれば組織内で無制限に利用できるのか? 5. これらの車には何らかのセーフティ認証が付いていますか? よろしくお願いいたします。 ドゥルガ・チョードリー Re: Question about S32 Safety Software Framework (SAF) and Safety Peripheral Drivers (SPD) こんにちは、ドゥルガ・チョードリーさん。 1. RTDを補完/強化する。The SPD 製品ブリーフ and SAF 製品ブリーフ mentions “complements the S32 リアルタイム・ドライバ (RTD)” to cover safety-related on-chip ペリフェラル, and other NXP material says SPD SAF requires/targets specific compatible RTD パッケージ rather than replacing them. 2. はい。S32K3 SAFの納品物には「ソースコード、ユーザーマニュアル、SAFデモアプリケーション」と記載されており、S32K3 SPD納品物にも同様に「ソースコード、ユーザーマニュアル、SPDデモアプリケーション」と記載されています。 3.4.どうか選んだ 代理店と連絡してください。 5. 機能安全プロセスのコンプライアンスと安全関連の資料が付属しており、ECUやシステムの自動認証は含まれていません。 SAFはISO 26262機能安全準拠とされ、SEooCとして開発され、ASIL Dまでの統合に利用可能です。 SPDの資料にも同様に、ISO 26262機能安全基準(ASIL D)への準拠が記載されています。 セーフティパッケージには 、SAFセーフティマニュアル、セーフティ分析、FMEA、故障カバレッジ推定が含まれます。SAF/SPDをダウンロードする際には、 SW32K3_SPD_1.0.6_SafetyPack.zipのようなものをダウンロードできます。 よろしくお願いいたします ロビン Re: Question about S32 Safety Software Framework (SAF) and Safety Peripheral Drivers (SPD) こんにちは、 @Robin_Shen さん。 ご説明ありがとうございます。トピック3と4について:私たちはアメリカ合衆国に拠点を置く会社です。つまり、ライセンスを(もし購入するなら)代理店から購入するということですか?Digikeyのサイトを試してみたところ、このトピックに関するあなたのサイトに戻ってきました。具体的な連絡先情報(URL/メールアドレスなど)を教えていただけますか? よろしくお願いいたします。 ドゥルガ・チョードリー Re: Question about S32 Safety Software Framework (SAF) and Safety Peripheral Drivers (SPD) SPDは無料です。 NXPはSAF評価版の提供を終了しました。完全版のSAFは、NDA(秘密保持契約)を条件として、開発目的のみで利用可能になりました。 以下は内部チームから受け取った情報です: SAFの開発ライセンスを取得したいお客様は、それぞれの代理店を通じて手続きを進めるべきです。代理店はNXPの担当者と直接連絡を取り、お客様に見積もりを発行できます。顧客が条件を受け入れれば、ソフトウェアが提供されます。 Re: Question about S32 Safety Software Framework (SAF) and Safety Peripheral Drivers (SPD) こんにちは、 @Robin_Shen さん。 最新情報ありがとうございます。あなたの発言に基づくと、私の理解は以下のとおりです。 1. 承認されたディーラーの誰かに連絡します(特定の連絡先、例えばメールで連絡すると助かります) 2. 彼ら(あるいはNXP?)とNDAを締結する。 3. ソフトウェア(SAFとSPDの両方)は無料で提供されます。 私の理解が正しいか確認していただけますか? 最高、 ドゥルガー 私の Re: Question about S32 Safety Software Framework (SAF) and Safety Peripheral Drivers (SPD) ご対応ありがとうございます。 Re: Question about S32 Safety Software Framework (SAF) and Safety Peripheral Drivers (SPD) NXP社と機密保持契約を締結する。秘密保持契約(NDA)についてもっと詳しく知りたい方はこちらをご覧ください(よくある質問) 。 秘密保持契約(NDA)を申請する お住まいの 地元の代理店のウェブサイトをご覧ください。通常、電話番号とメールアドレスが記載される「お問い合わせ」ボタンがあります。 SPDは無料です。SAFのウェブページによると、「 SW32K3M-SAF-DL S32K3-S32M27x SAF開発非製品ライセンス(1年間) 」の評価期間は1年間です。制作ライセンスの購入が必要な場合は、代理店にお問い合わせください。
查看全文
S32K3用のAES_ACCELサブシステムRMはどこで入手できますか? こんにちは、NXP 現在、 AES_ACCELモジュールの使い方を学んでいます。S32K3リファレンスマニュアルやHSEリファレンスマニュアルにはあまり情報が見つかりませんでした。AES_ACCELサブシステムリファレンス・マニュアルドキュメントには専用が記載されていますが、NXPのウェブサイトでは見つけられませんでした。リンクを教えていただけるか、ダウンロードできる場所を教えていただけませんか? wuxianlong_0-1782900693587.png 前もって感謝します。 シアンロン Re: Where to find AES_ACCEL Subsystem RM for S32K3? こんにちは@wuxianlong プライベートメッセージを送りました。
查看全文
ls1028ardb yocto-sdk build problems Hi, I'm trying to follow the instructions here: https://github.com/nxp-qoriq/yocto-sdk to build the OS and SDK images for the LS1028ARDB It appears that walnascar is the default branch, but the build fails if i use the instructions at the link above. mkdir yocto-sdk cd yocto-sdk repo init -u https://github.com/nxp-qoriq/yocto-sdk -b walnascar repo sync --force-sync . ./setup-env -m ls1028ardb bitbake fsl-image-networking this fails with 3 errors: - sysvinit installation errors - dtc-native compile errors - util-linux-native compile errors I've also tried the instructions from this document which fail in a different way even if you work around the incorrect instructions (the specified "ls-image-desktop" does not exist): https://docs.nxp.com/bundle/UG10081_LLDP_L6.1.55_2.2.0/page/topics/how_to_download_flexbuild.html I also found the flexbuild option, and followed the instructions here: https://github.com/nxp/flexbuild git clone https://github.com/NXP/flexbuild.git cd flexbuild make docker make ls1028ardb_defconfig make all this also fails with the error: W: binfmt_misc not found in /proc/mounts -- not mounted What are the correct instructions for building the OS image and SDK? Regards Matt Re: ls1028ardb yocto-sdk build problems Please use the following latest Yocto Linux SDK release. The release includes both source code and prebuilt images as listed below: Source Release files are on https://github.com/nxp-qoriq/yocto-sdk/tree/walnascar-lsdk Branch: walnascar-lsdk Linux BSP Supported boards, Features, Known Issues, please refer to Release Notes Layerscape Software Development Kit User Guide for Yocto: UG10374.pdf Layerscape Linux SDK User Guide: UG10381.pdf The following precompiled images are hosted on https://www.nxp.com/lgfiles/llsdk/walnascar/ > # Name Description 1 boot_ls1028ardb_lts_6.12.tgz Bootpartition image for LS1028ARDB 2 boot_ls1043ardb_lts_6.12.tgz Bootpartition image for LS1043ARDB 3 boot_ls1046ardb_lts_6.12.tgz Bootpartition image for LS1046ARDB 4 boot_lx2160ardb-rev2_lts_6.12.tgz Bootpartition image for LX2160ARDB 5 firmware_ls1028ardb_uboot_emmcboot.img BSP firmware image for LS1028ARDB eMMC boot 6 firmware_ls1028ardb_uboot_sdboot.img BSP firmware image for LS1028ARDB SD boot 7 firmware_ls1028ardb_uboot_xspiboot.img BSP firmware image for LS1028ARDB XSPI boot 8 firmware_ls1043ardb_uboot_nandboot.img BSP firmware image for LS1043ARDB NAND boot 9 firmware_ls1043ardb_uboot_norboot.img BSP firmware image for LS1043ARDB NOR boot 10 firmware_ls1043ardb_uboot_sdboot.img BSP firmware image for LS1043ARDB SD boot 11 firmware_ls1046ardb_uboot_emmcboot.img BSP firmware image for LS1046ARDB eMMC boot 12 firmware_ls1046ardb_uboot_qspiboot.img BSP firmware image for LS1046ARDB QSPI boot 13 firmware_ls1046ardb_uboot_sdboot.img BSP firmware image for LS1046ARDB SD boot 14 firmware_lx2160ardb-rev2_uboot_emmcboot.img BSP firmware image for LX2160ARDB eMMC boot 15 firmware_lx2160ardb-rev2_uboot_sdboot.img BSP firmware image for LX2160ARDB SD boot 16 firmware_lx2160ardb-rev2_uboot_xspiboot.img BSP firmware image for LX2160ARDB xSPI boot 17 fsl-image-networking-ls1028ardb.rootfs.tar.gz Layerscape rootfs supports basic networking functionality on LS1028ARDB 18 fsl-image-networking-full-ls1028ardb.rootfs.tar.gz Layerscape rootfs supports full networking functionality on LS1028ARDB 19 fsl-image-networking-ls1043ardb.rootfs.tar.gz Layerscape rootfs supports basic networking functionality on LS1043ARDB 20 fsl-image-networking-full-ls1043ardb.rootfs.tar.gz Layerscape rootfs supports full networking functionality on LS1043ARDB 21 fsl-image-networking-ls1046ardb.rootfs.tar.gz Layerscape rootfs supports basic networking functionality on LS1046ARDB 22 fsl-image-networking-full-ls1046ardb.rootfs.tar.gz Layerscape rootfs supports full networking functionality on LS1046ARDB 23 fsl-image-networking-lx2160ardb-rev2.rootfs.tar.gz Layerscape rootfs supports basic networking functionality on LX2160ARDB 24 fsl-image-networking-full-lx2160ardbrev2.rootfs.tar.gz Layerscape rootfs supports full networking functionality on LX2160ARDB 25 flex-installer Deploy tools Please refer to the User Guide document for the detailed steps of image deployment. You also could use Debian flexbuilder Linux SDK to use Debian Linux OS.  Re: ls1028ardb yocto-sdk build problems after posting this, I discovered Debian Linux SDK User Guide which has some pre-requisites not listed in the flexbuild readme.md. This appears to allow me to generate a Debian based image for the LS1028ARDB.  What are the instructions for generating an SDK in a similar way to the Yocto environment? or do you recommend a standard cross-compiler? Is the Debian solution now the recommended OS for this platform? Yocto feels more appropriate for an embedded system. Regards Matt Re: ls1028ardb yocto-sdk build problems Hi, Thanks for the input but the walnascar-lsdk branch fails with similar errors as the walnascar branch i described above. This is the output for bitbake -k fsl-image-networking-full Summary: 4 tasks failed: ~/walnascar-lsdk/sources/poky/meta/recipes-core/sysvinit/sysvinit-inittab_2.88dsf.bb:do_install log: ~/walnascar-lsdk/build_ls1028ardb/tmp/work/ls1028ardb-fsl-linux/sysvinit-inittab/2.88dsf/temp/log.do_install.1267212 virtual:native:~/walnascar-lsdk/sources/poky/meta/recipes-core/util-linux/util-linux_2.40.4.bb:do_compile log: ~/walnascar-lsdk/build_ls1028ardb/tmp/work/x86_64-linux/util-linux-native/2.40.4/temp/log.do_compile.1304034 virtual:native:~/walnascar-lsdk/sources/poky/meta/recipes-kernel/dtc/dtc_1.7.2.bb:do_compile log: ~/walnascar-lsdk/build_ls1028ardb/tmp/work/x86_64-linux/dtc-native/1.7.2/temp/log.do_compile.1321834 ~/walnascar-lsdk/sources/poky/meta/recipes-devtools/flex/flex_2.6.4.bb:do_compile log: ~/walnascar-lsdk/build_ls1028ardb/tmp/work/aarch64-fsl-linux/flex/2.6.4/temp/log.do_compile.2409352 Summary: There were 17 WARNING messages. Summary: There were 6 ERROR messages, returning a non-zero exit code. Regards Matt Re: ls1028ardb yocto-sdk build problems Hi, Thanks for the reply, it turns out it was my fault, I was using the wrong version of ubuntu and stupidly ignored the warning in the yocto output. I switched to using a 24.04 dev container and following the instructions in: Layerscape Software Development Kit User Guide for Yocto: UG10374.pdf to do the build and that worked fine. Regards Matt Re: ls1028ardb yocto-sdk build problems Please install the host packages as the following. sudo apt-get install build-essential chrpath cpio debianutils diffstat file gawk gcc git iputils-ping libacl1 liblz4-tool locales python3 python3-git python3- jinja2 python3-pexpect python3-pip python3-subunit socat texinfo unzip wget xzutils zstd efitools If your problem persists, please send the log file ~/walnascar-lsdk/build_ls1028ardb/tmp/work/ls1028ardb-fsl-linux/sysvinit-inittab/2.88dsf/temp/log.do_install.1267212 to me to do investigation.
查看全文
Enabling Multicore Application on S32G3 using S32G3 Platform Software Integration Hello;  We are trying to reproduce the steps on doc AN13750 applied to the S32G399a, our concern is regarding the build of the IPCF modules.  In the doc it is said to use the "0001-ipc-multi-instances.patch" but this is not applicable on the S32G3  TrikiIkram_0-1782919427268.png Is there a way to explain to us how to proceed the build of the IPCF modules in the case of the S32G3 in order to be able to go through all the steps in the document and succeed the dual boot. Re: Enabling Multicore Application on S32G3 using S32G3 Platform Software Integration Hello, @TrikiIkram  Thanks for your post. 1. Sorry that there is still not a public document for your reference, which would act as a similar reference as AN13750 for S32G3. 2. Currently, I suggest using AN13750 as a reference, not a step-by-step guide for using it on S32G3, for setup the IPCF on S32G3 platform, I suggest directly trying the single instance samples instead of the multi-instance sample, so that you will not need apply the patch mentioned. BR Chenyin
查看全文
利用 S32G3 平台软件集成在 S32G3 上启用多核应用程序 你好; 我们正在尝试将文档 AN13750 中的步骤应用于 S32G399a,我们关注的是 IPCF 模块的构建。 文档中提到要使用“ 0001-ipc-multi-instances.patch ”。但这不适用于S32G3。 TrikiIkram_0-1782919427268.png 能否向我们解释一下,在 S32G3 的情况下,如何构建 IPCF 模块,以便能够按照文档中的所有步骤进行操作并成功实现双启动? Re: Enabling Multicore Application on S32G3 using S32G3 Platform Software Integration 你好, @TrikiIkram 感谢你的帖子。 1. 很抱歉,目前还没有公开文档供您参考,该文档可以作为 S32G3 的 AN13750 的类似参考。 2. 目前,我建议使用 AN13750 作为参考,而不是在 S32G3 上使用它的分步指南。对于在 S32G3 平台上设置 IPCF,我建议直接尝试单实例示例,而不是多实例示例,这样您就不需要应用提到的补丁了。 BR 陈银
查看全文
哪里可以找到适用于 S32K3 的 AES_ACCEL 子系统 RM? 您好,NXP 我目前正在学习如何使用AES_ACCEL模块。我在S32K3 参考手册或HSE 参考手册中都找不到太多信息。文档中提到有专门的AES_ACCEL 子系统参考手册,但我没能在 NXP 网站上找到它。请问能否提供下载链接或告知下载地点? wuxianlong_0-1782900693587.png 提前致谢。 显龙 Re: Where to find AES_ACCEL Subsystem RM for S32K3? 嗨@wuxianlong 我给你发了私信。
查看全文