2389035_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2389035_en-US

2389035_en-US

ls1028ardb yocto-sdk build problems

Hi,

I'm trying to follow the instructions here:

https://github.com/nxp-qoriq/yocto-sdk

to build the OS and SDK images for the LS1028ARDB

It appears that walnascar is the default branch, but the build fails if i use the instructions at the link above.

mkdir yocto-sdk
cd yocto-sdk
repo init -u https://github.com/nxp-qoriq/yocto-sdk -b walnascar
repo sync --force-sync
. ./setup-env -m ls1028ardb
bitbake fsl-image-networking

this fails with 3 errors:
- sysvinit installation errors
- dtc-native compile errors
- util-linux-native compile errors

I've also tried the instructions from this document which fail in a different way even if you work around the incorrect instructions (the specified "ls-image-desktop" does not exist):

https://docs.nxp.com/bundle/UG10081_LLDP_L6.1.55_2.2.0/page/topics/how_to_download_flexbuild.html

I also found the flexbuild option, and followed the instructions here:

https://github.com/nxp/flexbuild

git clone https://github.com/NXP/flexbuild.git
cd flexbuild
make docker
make ls1028ardb_defconfig
make all

this also fails with the error:

W: binfmt_misc not found in /proc/mounts -- not mounted

What are the correct instructions for building the OS image and SDK?

Regards

Matt

Re: ls1028ardb yocto-sdk build problems

Please use the following latest Yocto Linux SDK release.

The release includes both source code and prebuilt images as listed below:

Branch: walnascar-lsdk

#

Name

Description

1

boot_ls1028ardb_lts_6.12.tgz

Bootpartition image for LS1028ARDB

2

boot_ls1043ardb_lts_6.12.tgz

Bootpartition image for LS1043ARDB

3

boot_ls1046ardb_lts_6.12.tgz

Bootpartition image for LS1046ARDB

4

boot_lx2160ardb-rev2_lts_6.12.tgz

Bootpartition image for LX2160ARDB

5

firmware_ls1028ardb_uboot_emmcboot.img

BSP firmware image for LS1028ARDB eMMC boot

6

firmware_ls1028ardb_uboot_sdboot.img

BSP firmware image for LS1028ARDB SD boot

7

firmware_ls1028ardb_uboot_xspiboot.img

BSP firmware image for LS1028ARDB XSPI boot

8

firmware_ls1043ardb_uboot_nandboot.img

BSP firmware image for LS1043ARDB NAND boot

9

firmware_ls1043ardb_uboot_norboot.img

BSP firmware image for LS1043ARDB NOR boot

10

firmware_ls1043ardb_uboot_sdboot.img

BSP firmware image for LS1043ARDB SD boot

11

firmware_ls1046ardb_uboot_emmcboot.img

BSP firmware image for LS1046ARDB eMMC boot

12

firmware_ls1046ardb_uboot_qspiboot.img

BSP firmware image for LS1046ARDB QSPI boot

13

firmware_ls1046ardb_uboot_sdboot.img

BSP firmware image for LS1046ARDB SD boot

14

firmware_lx2160ardb-rev2_uboot_emmcboot.img

BSP firmware image for LX2160ARDB eMMC boot

15

firmware_lx2160ardb-rev2_uboot_sdboot.img

BSP firmware image for LX2160ARDB SD boot

16

firmware_lx2160ardb-rev2_uboot_xspiboot.img

BSP firmware image for LX2160ARDB xSPI boot

17

fsl-image-networking-ls1028ardb.rootfs.tar.gz

Layerscape rootfs supports basic networking functionality on LS1028ARDB

18

fsl-image-networking-full-ls1028ardb.rootfs.tar.gz

Layerscape rootfs supports full networking functionality on LS1028ARDB

19

fsl-image-networking-ls1043ardb.rootfs.tar.gz

Layerscape rootfs supports basic networking functionality on LS1043ARDB

20

fsl-image-networking-full-ls1043ardb.rootfs.tar.gz

Layerscape rootfs supports full networking functionality on LS1043ARDB

21

fsl-image-networking-ls1046ardb.rootfs.tar.gz

Layerscape rootfs supports basic networking functionality on LS1046ARDB

22

fsl-image-networking-full-ls1046ardb.rootfs.tar.gz

Layerscape rootfs supports full networking functionality on LS1046ARDB

23

fsl-image-networking-lx2160ardb-rev2.rootfs.tar.gz

Layerscape rootfs supports basic networking functionality on LX2160ARDB

24

fsl-image-networking-full-lx2160ardbrev2.rootfs.tar.gz

Layerscape rootfs supports full networking functionality on LX2160ARDB

25

flex-installer

Deploy tools


Please refer to the User Guide document for the detailed steps of image deployment.


You also could use Debian flexbuilder Linux SDK to use Debian Linux OS. 

Re: ls1028ardb yocto-sdk build problems

after posting this, I discovered Debian Linux SDK User Guide which has some pre-requisites not listed in the flexbuild readme.md. This appears to allow me to generate a Debian based image for the LS1028ARDB. 

What are the instructions for generating an SDK in a similar way to the Yocto environment? or do you recommend a standard cross-compiler?

Is the Debian solution now the recommended OS for this platform? Yocto feels more appropriate for an embedded system.

Regards

Matt

Re: ls1028ardb yocto-sdk build problems

Hi,

Thanks for the input but the walnascar-lsdk branch fails with similar errors as the walnascar branch i described above.

This is the output for
bitbake -k fsl-image-networking-full

Summary: 4 tasks failed:
~/walnascar-lsdk/sources/poky/meta/recipes-core/sysvinit/sysvinit-inittab_2.88dsf.bb:do_install
log: ~/walnascar-lsdk/build_ls1028ardb/tmp/work/ls1028ardb-fsl-linux/sysvinit-inittab/2.88dsf/temp/log.do_install.1267212
virtual:native:~/walnascar-lsdk/sources/poky/meta/recipes-core/util-linux/util-linux_2.40.4.bb:do_compile
log: ~/walnascar-lsdk/build_ls1028ardb/tmp/work/x86_64-linux/util-linux-native/2.40.4/temp/log.do_compile.1304034
virtual:native:~/walnascar-lsdk/sources/poky/meta/recipes-kernel/dtc/dtc_1.7.2.bb:do_compile
log: ~/walnascar-lsdk/build_ls1028ardb/tmp/work/x86_64-linux/dtc-native/1.7.2/temp/log.do_compile.1321834
~/walnascar-lsdk/sources/poky/meta/recipes-devtools/flex/flex_2.6.4.bb:do_compile
log: ~/walnascar-lsdk/build_ls1028ardb/tmp/work/aarch64-fsl-linux/flex/2.6.4/temp/log.do_compile.2409352
Summary: There were 17 WARNING messages.
Summary: There were 6 ERROR messages, returning a non-zero exit code.

Regards
Matt

Re: ls1028ardb yocto-sdk build problems

Hi,

Thanks for the reply, it turns out it was my fault, I was using the wrong version of ubuntu and stupidly ignored the warning in the yocto output.

I switched to using a 24.04 dev container and following the instructions in:

  • Layerscape Software Development Kit User Guide for Yocto: UG10374.pdf

to do the build and that worked fine.

Regards

Matt

Re: ls1028ardb yocto-sdk build problems

Please install the host packages as the following.

sudo apt-get install build-essential chrpath cpio debianutils diffstat file gawk

gcc git iputils-ping libacl1 liblz4-tool locales python3 python3-git python3-

jinja2 python3-pexpect python3-pip python3-subunit socat texinfo unzip wget xzutils

zstd efitools

If your problem persists, please send the log file ~/walnascar-lsdk/build_ls1028ardb/tmp/work/ls1028ardb-fsl-linux/sysvinit-inittab/2.88dsf/temp/log.do_install.1267212 to me to do investigation.

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎07-08-2026 02:29 AM
更新者: