Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
IMX8QXP RAM ECC 我的 i.MX 8QXP 板配置为使用边带 ECC 模式。是否有支持此功能并能检测 ECC 错误的 Linux 驱动程序?我在《应用处理器参考手册》(PRM)中没有找到任何与 ECC 相关的寄存器。 谢谢。 MCXC Re: IMX8QXP RAM ECC 你好@qwerty1123 我们尚未发布ECC的验证模块。您需要自行编写验证程序。请参考以下文档。 https://www.nxp.com/docs/en/application-note/AN13566.pdf 您可以参考 IMX8DXL RM 了解 ECC 寄存器的相关内容。imx8qxp 和 imx8dxl 使用相同的 DDRC IP。 B.R Re: IMX8QXP RAM ECC @qwerty1123 ECC 可以启用,DDRC 硬件也可以检测错误,但除非您拥有已获取源代码之外的 电路板支持包/私有补丁,否则不应期望找到适用于 i.MX 8QXP 边带 ECC 的现有 Linux EDAC 驱动程序。板级驱动程序需要映射AN13566中的 DDRC ECC 寄存器,并处理 ECC_CORRECT_INT  / ECC_NCORRECT_INT  读取 ECCSTAT  / ECCERRCNT  清晰地通过 ECCCTL  并可选择向 Linux EDAC 框架注册。 该应用笔记描述了通过 DDRC 寄存器实现可纠正中断、不可纠正中断和 AP 错误中断的使能和状态处理。所以,你很可能需要为此编写一个自定义驱动程序。
View full article
IMX8QXP RAM ECC My i.MX 8QXP board is configured to use sideband ECC mode. Is there a Linux driver available that supports this and can detect ECC errors? I haven't found any ECC-related registers in the Applications Processor Reference Manual (PRM). THANKS. MCXC Re: IMX8QXP RAM ECC Hi @qwerty1123  We have not yet released a verification module for ECC. You will need to write your own verification program. Please refer to the documentation below. https://www.nxp.com/docs/en/application-note/AN13566.pdf You can refer IMX8DXL RM about ECC register. imx8qxp and imx8dxl use the same DDRC IP.  B.R Re: IMX8QXP RAM ECC @qwerty1123  ECC can be enabled and errors can be detected by the DDRC hardware, but you should not expect an existing Linux EDAC driver for i.MX 8QXP sideband ECC unless you have a BSP/private patch outside the retrieved sources. A board-specific driver would need to map the DDRC ECC registers from AN13566, handle  ECC_CORRECT_INT  /  ECC_NCORRECT_INT  , read  ECCSTAT  /  ECCERRCNT  , clear through  ECCCTL  , and optionally register with the Linux EDAC framework. The app note describes correctable, uncorrectable, and AP error interrupt enables and status handling through DDRC registers. So, you most probably have to write a custom driver for it.
View full article
The program malfunctioned after encryption with imxrt1050 bee. The program is simply a timer program that makes an LED blink. It runs normally on an unencrypted board, but it doesn't run on an encrypted board after encryption. I don't know how to troubleshoot this. The J-Link can't connect either, making troubleshooting even more difficult. I'm using AXF or HEX image files. In the program used by FDCB, because the DQS pin is used, QSPI is set to 50M, and CSStepUp/Hold is set to 2. Snipaste_2026-08-19_11-10-50.pngSnipaste_2026-08-19_11-10-50.png Snipaste_2026-08-19_11-11-26.pngSnipaste_2026-08-19_11-11-26.png Snipaste_2026-08-19_11-12-16.pngSnipaste_2026-08-19_11-12-16.png i.MXRT 105x Re: imxrt1050 bee加密后程序运行异常 Hi @ccc_clive , I noticed you're using OTPMK, which is the SNVS key, as the key. However, this key is only valid when HAB is closed; otherwise, it's all zeros. Try the signed encrypted XIP mode to see if you get a different result. Additionally, our experts have discussed similar situations in previous articles; for details, please refer to "If i.MXRT1xxx fails to start offline, please first check the SRC_SBMRx register". Best Regards, Kan Re: imxrt1050 bee加密后程序运行异常 You can erase everything and re-download, but it won't look like anything has changed. Re: imxrt1050 bee加密后程序运行异常 Hi @ccc_clive , Can you change the board's boot mode to serial download? If so, use SPT or MCUBootUtilities to perform a mass erase and see if you can re-flash the image. Best Regards, Kan
View full article
imxrt1050 bee加密后程序运行异常 就一个定时器里面的led闪烁的程序,不加密时在非加密的板上运行正常,加密后在加密的板上没运行,这不知道如何去排查了,jlink也链接不上了,更加无法排查了。镜像文件选axf或者hex。fdcb使用的程序中的,因为dqs脚被用了,所以qspi设置的50M的,csstepup/hold都设置的2 Snipaste_2026-08-19_11-10-50.pngSnipaste_2026-08-19_11-10-50.png Snipaste_2026-08-19_11-11-26.pngSnipaste_2026-08-19_11-11-26.png Snipaste_2026-08-19_11-12-16.pngSnipaste_2026-08-19_11-12-16.png i.MXRT 105x Re: imxrt1050 bee加密后程序运行异常 Hi @ccc_clive , 我注意到你用OTPMK,即 SNVS key作为密钥,但这个key只在 HAB 为 close 时才有效,不然是全0,你试试signed encrypted XIP模式会不会有不一样的结果。 另外我们的专家以前分享的文章中也讲到了相似的情况,具体可参考如果i.MXRT1xxx离线无法启动,请先查看SRC_SBMRx寄存器 Best Regards, Kan Re: imxrt1050 bee加密后程序运行异常 可以全部擦除重新下载,但是看着没啥改变的样子 Re: imxrt1050 bee加密后程序运行异常 Hi @ccc_clive , 能把板子的boot mode改成serial download吗?可以的话用spt或者mcubootutilities去mass erase,看看能不能重新烧录image。 Best Regards, Kan
View full article
imxrt1050 beeによる暗号化後、プログラムが誤動作しました。 このプログラムは、LEDを点滅させるだけのタイマープログラムです。暗号化されていないボードでは正常に動作しますが、暗号化されたボードでは暗号化後に動作しません。この問題のトラブルシューティング方法がわかりません。J-Linkも接続できないため、トラブルシューティングはさらに困難です。AXFまたはHEXイメージファイルを使用しています。FDCBで使用されるプログラムでは、DQSピンが使用されているため、QSPIは50Mに設定され、CSStepUp/Holdは2に設定されています。 Snipaste_2026-08-19_11-10-50.pngSnipaste_2026-08-19_11-10-50.png Snipaste_2026-08-19_11-11-26.pngSnipaste_2026-08-19_11-11-26.png Snipaste_2026-08-19_11-12-16.pngSnipaste_2026-08-19_11-12-16.png i.MXRT 105x Re: imxrt1050 bee加密后程序运行异常 こんにちは、 @ccc_clive さん。 SNVSキーであるOTPMKをキーとして使用しているようですが、このキーはHABが閉じている場合にのみ有効で、それ以外の場合はすべてゼロになります。署名付き暗号化XIPモードを試して、結果が異なるかどうか確認してください。 さらに、当社の専門家は以前の記事で同様の状況について解説しています。詳細については、 「i.MXRT1xxxがオフラインで起動しない場合は、まずSRC_SBMRxレジスタを確認してください」を参照してください。 よろしくお願いします、 カン Re: imxrt1050 bee加密后程序运行异常 すべて消去して再ダウンロードすることはできますが、見た目には何も変わっていないように見えます。 Re: imxrt1050 bee加密后程序运行异常 こんにちは、 @ccc_clive さん、 ボードのブートモードをシリアルダウンロードに変更できますか?もし可能であれば、SPTまたはMCUBootUtilitiesを使用して一括消去を実行し、イメージを再フラッシュできるかどうか確認してください。 よろしくお願いします、 カン
View full article
IMX8MQヨクト、ゼウス、えっと。 hi 私はimx8mq-evkを使用しました。 Yocto[Zeus] カーネルバージョン。5.4.70_2.3.0 YOCTOのビルドを完成させ、SDカードに統合してから実行しました。 以下のエラーが発生したようですが、解決方法がわかりません。助けてくれないか? U-Boot SPL 2020.04-5.4.70-2.3.0+ge42dee8(2021年1月27日 08:29:45 +0000) PMIC: PFUZE100 ID=0x10 DDRINFO: DRAM初期化を開始します DDRINFO: DRAMレート 3200MTS DDRINFO: DDRHYキャリブレーション完了 DDRINFO: ddrmix 設定完了 通常起動 MMC2から起動しようとしています E/TC:0 0 caam_mp_init:364 ************************************ E/TC:0 0 caam_mp_init:365 * 警告: 製造上の保護 * E/TC:0 0 caam_mp_init:366 * はサポートされていません * E/TC:0 0 caam_mp_init:367 ************************************ U ブート 2020.04-5.4.70-2.3.0+ge42dee8(2021年1月27日 08:29:45 +0000) CPU:i.MX8MQ rev2.0 1500 MHz(1000 MHzで動作) CPU:市販温度グレード(0°Cから95°C)、57°Cで対応 リセット原因:POR(POR) モデル:NXP i.MX8MQ EVK DRAM:3 GiB TCPC:ベンダーID [0x1fc9]、製品ID [0x5110]、Addr [I2C0 0x50] MMC: FSL_SDHC: 0, FSL_SDHC: 1 MMCからの読み込み環境...CMD11 1.8Vスイッチを使います 警告 - CRCが悪い、デフォルト環境を使用しています [*]-ビデオリンク 0imx8m_hdmi_probe (1280 x 720) [0] ディスプレイコントローラー@32e00000、ビデオ [1] hdmi@32c00000、ディスプレイ 掲載: シリアル 出力: シリアル エラー: シリアル ビルド情報: - ATF f1d7187 - U-Boot 2020.04-5.4.70-2.3.0+ge42dee8 CMD11 1.8Vスイッチを使います パーティション#0に切り替える、OK MMC1は現在のデバイスです フラッシュターゲットはMMC:1です CMD11 1.8Vスイッチを使います ネット: エラー:ethernet@30be0000アドレスが設定されていません。 エラー: ethernet@30be0000 アドレスが設定されていません。 イーサネットは見つかりませんでした。 速攻:通常 ノーマルブート どのキーを押してもオートブートを止める:0 CMD11 1.8V スイッチ パーティション#0にスイッチ、OK MMC1は現在のデバイスです CMD11 1.8V スイッチ 28013056バイトの読み取り速度は449ms(59.5 MiB/s) MMCから起動中... 45027バイトを23ms(1.9 MiB/s)で読み取る ## 430000000で平坦なデバイスツリーの塊 0x43000000のFDTブロブを使って起動します デバイスツリーを0000000043000000で使用し、終了時の000000004300dfe2 カーネルを起動中… [ 0.000000] 物理CPUでLinuxを起動0x0000000000 [0x410fd034] [ 0.000000] Linuxバージョン 5.4.70-2.3.0+g4f2631b(OE-user@oeホスト)(gccバージョン9.2.0(GCC))#1 SMP PREEMPT 2005年1月28日(木) :36:23 UTC 2021年 [ 0.000000] 機種:NXP i.MX8MQ EVK [ 0.00000] EFI:FDTからEFIパラメータを取得する: [ 0.000000] EFI: UEFIが見つかりません。 [ 0.00000] 予約メモリ:0x0000000044000000でCMAメモリプールを作成、サイズ960 MiBで [ 0.00000] OF: 予約済みメモリ:初期化されたNode Linux、CMA、互換性ID Shared-DMA-プール [0.000000] NUMA:NUMA構成は検出されませんでした [0.000000] NUMA: [mem 0x0000000040000000-0x00000000fdffffff] でノードを偽装中 [0.000000] ヌマ:NODE_DATA [記憶0xfd9de500-0xfd9dffff] [ 0.000000] ゾーン範囲: [0.000000] DMA32 [記憶0x0000000040000000-0x00000000fdffffff] [ 0.000000] ノーマル 空 [ 0.000000] 各ノードの可動域開始 [ 0.000000] 初期のメモリノード範囲 [ 0.000000] ノード0: [記憶 0x0000000040000000-0x00000000b7ffffff] [ 0.000000] ノード0: [記憶 0x00000000b8400000-0x00000000fdffffff] [ 0.000000] イニシテムセットアップノード0 [メモリ0x0000000040000000-0x00000000fdffffff] [ 0.000000] PSCI:DTからの導管のプロービング方法。 [ 0.000000] PSCI:ファームウェアでPSCIv1.1を検出。 [ 0.000000] psci:標準PSCI v0.2機能IDの使用 [ 0.000000] psci: 信頼できるOS移行は不要 [ 0.00000] psci: SMC Calling Convention v1.1 [ 0.000000] percpu: 組み込み 24ページ/cpu s58904 r8192 d31208 u98304 [ 0.000000] CPU0でVIPT Iキャッシュを検出 [ 0.000000] CPU機能:検出:ARMエラタム845719 [ 0.000000] CPU機能:検出:GICシステムレジスタCPUインターフェース [ 0.000000] 投機的なストアバイパス 無効化緩和は不要 [ 0.00000] ゾーンリストを1つ作成、モビリティグループオン。総ページ数:765056 [ 0.000000] ポリシーゾーン:DMA32 [ 0.000000] カーネルコマンドライン: console=ttymxc0,115200 root=/dev/mmcblk1p2 rootwait rw [ 0.00000] Dentry キャッシュ ハッシュテーブルエントリ:524288(順序:10、4194304バイト、線形) [ 0.000000] Inodeキャッシュハッシュテーブルエントリ:262144(順序:9、2097152バイト、線形) [ 0.000000] mem auto-init: stack:off、heap alloc:off、heap free:off [ 0.000000] メモリ:2035416K/3108864Kが利用可能(カーネルコード16636K、rwdata1244K、rodata6556K、2880K初init、1017K BSS、 90408K予約、983040K CMA予約) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1 [ 0.000000] rcu:プリエンプティブ階層的RCU実装。 [ 0.000000] rcu: RCU は CPU を NR_CPUS=256 から nr_cpu_ids=4 に制限します。 [ 0.000000] タスク RCU が有効になりました。 [ 0.000000] rcu: RCU が計算したスケジューラ登録遅延の値は 25 ジフィーです。 [ 0.000000] rcu: rcu_fanout_leaf=16、nr_cpu_ids=4 のジオメトリ調整 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, 事前割り当てIRQ: 0 [ 0.000000] GICv3: GIC:分割EOI/無効化モードの使用 [ 0.000000] GICv3:128 SPIの実装 [ 0.000000] GICv3: 0 拡張SPIの実装 [ 0.000000] GICv3: ディストリビューターにはレンジセレクタのサポートがない [ 0.000000] GICv3:16 PPIの実装 [ 0.000000] GICv3:VLPI対応なし、LPI直接サポートなし [ 0.000000] GICv3: CPU0: リディストリビューター0 リージョン0:0x0000000038880000 [ 0.000000] ITS: ITSは利用できません。LPIが有効化されていません [ 0.000000] ランダム:get_random_bytes start_kernel+0x2b8/0x44cからcrng_init=0で呼び出されます [ 0.00000] arch_timer:8.33MHz(物理)で動作するCP15タイマー。 [ 0.00000] クロックソース:arch_sys_counter: マスク: 0xffffffffffffff max_cycles: 0x1ec0311ec, max_idle_ns: 440795202152 ns [ 0.000004] sched_clock:56ビット、8MHz、解像度120ns、2199023255541nsごとにラップ [ 0.000489] コンソール:カラーダミーデバイス 80x25 [ 0.000562] 遅延ループのキャリブレーション(スキップ)、タイマー周波数で値を計算...16.66 BogoMIPS (lpj=3333) [ 0.000573] pid_max: デフォルト: 32768 最低: 301 [ 0.000658] LSM:セキュリティフレームワークの初期化 [ 0.000728] マウントキャッシュハッシュテーブルエントリ数:8192(順序:4,65536バイト、線形) [ 0.000751] マウントポイントキャッシュハッシュテーブルエントリ数:8192(順序:4,65536バイト、線形) [ 0.002075] ASIDアロケータが32768エントリで初期化 [ 0.002156] rcu:階層的SRCU実装。 [ 0.003208] EFI サービスは利用できません。 [ 0.003394] SMP: セカンダリCPUを起動中... [ 0.003822] CPU1でVIPT Iキャッシュを検出 [ 0.003847] GICv3: CPU1: リディストリビューター1 領域0:0x00000000388a0000 [ 0.003871] CPU1: セカンダリプロセッサを起動0x0000000001 [0x410fd034] [ 0.004361] CPU2でVIPT Iキャッシュを検出 [ 0.004379] GICv3: CPU2: リディストリビューター2 リージョン0:0x00000000388c0000 [ 0.004396] CPU2: セカンダリプロセッサを起動0x0000000002 [0x410fd034] [ 0.004824] CPU3でVIPT Iキャッシュを検出 [ 0.004842] GICv3: CPU3: リディストリビューター3 リージョン0:0x00000000388e0000 [ 0.004859] CPU3: 起動されたセカンダリプロセッサ 0x0000000003 [0x410fd034] [ 0.004928] smp: ノード1台、CPU4台を起動しました [0.004946] SMP:合計4つのプロセッサが起動。 [ 0.004955] CPU機能:検出済み:32ビットEL0サポート [ 0.004963] CPU機能:検出:CRC32命令 [ 0.013554] CPU:すべてのCPUはEL2からスタート [ 0.013580] 代替手段:カーネルコードのパッチ適用 [ 0.015195] devtmpfs: initialized [ 0.022456] 時計ソース:jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.022474] Futex ハッシュテーブルエントリ数:1024(順位数:4,65536バイト、線形) [ 0.051280] pinCtrl コア:initialized pinctrl subsystem [ 0.052146] DMIは存在しないか無効です。 [ 0.052428] NET: 登録プロトコルファミリ16 [ 0.059903] DMA:原子割り当て用に事前割り当てされた256 KiBプール [ 0.059919] 監査:NetLinkサブシステムの初期化(無効) [ 0.060075] 監査: タイプ=2000 監査(0.056:1):state=initialized audit_enabled=0 res=1 [ 0.061034] cpuidle: ガバナーメニューを使用しています [ 0.061540] hw-breakpoint: ブレークポイントレジスタが6個、ウォッチポイントレジスタが4個見つかりました。 [ 0.062493] シリアル:AMBA PL011 UARTドライバ [ 0.062565] IMX MUドライバが登録されています。 [ 0.062590] IMX RPMSGドライバーが登録されています。 [ 0.066577] imx8mq-pinctrl 30330000.iomuxc:IMX pinCtrlドライバーを初期化しました [ 0.092370] HugeTLBは登録済み 1.00 GiB ページサイズ、事前割り当て 0ページ [ 0.092380] HugeTLBは32.0 MiBページサイズで登録済み、事前割り当て0ページ [ 0.092389] HugeTLBは2.00 MiBページサイズで登録され、事前割り当て0ページ [ 0.092397] HugeTLBは登録済み 64.0 KiBページサイズ、事前割り当て 0ページ [ 0.093400] CRYPTD: max_cpu_qlen 1000に設定されている [ 0.096873] ACPI: 通訳が無効化されました。 [ 0.097770] iommu: デフォルトドメインタイプ: 翻訳済み [ 0.097932] vgaarb: ロード済み [ 0.098253] SCSIサブシステム初期化済み [ 0.098662] USBcore:登録済みの新しいインターフェースドライバー USBFS [ 0.098709] USBCORE:登録済みの新しいインターフェースドライバーハブ [ 0.098781] USBコア:登録済みの新しいデバイスドライバー USB [ 0.099843] mc: Linuxメディアインターフェース: v0.10 [ 0.099874] ビデオ開発:Linuxビデオキャプチャインターフェース:v2.00 [ 0.099944] pps_core: LinuxPPS API ver. 1 登録済み [ 0.099951] pps_core: ソフトウェア版5.3.6 - Copyright 2005-2007 Rodolfo Giometti [ 0.099967] PTPクロックサポート登録済み [ 0.100102] EDAC MC: バージョン: 3.0.0 [ 0.100903] BManポータルが利用できません! [ 0.101203] QMan: ルックアップテーブルを (__ __ptrval__ __) に割り当てました。エントリ数は 65537 です。 [ 0.101530] QManポータルが利用できません! [ 0.102010] USDPAAメモリがなく、デバイスツリーに「fsl、usdpaa-mem」もありません [ 0.102400] FPGAマネージャーフレームワーク [ 0.102498] 高度なLinuxサウンドアーキテクチャドライバーを初期化しました。 [ 0.102920] Bluetooth: Core ver 2.22 [ 0.102946] NET: 登録プロトコルファミリ31 [ 0.102951] Bluetooth:HCIデバイスと接続マネージャーの初期化 [ 0.102966] Bluetooth:HCIソケット層の初期化 [ 0.102974] Bluetooth:L2CAPソケット層の初期化 [ 0.102990 ] Bluetooth:SCOソケット層の初期化済み [ 0.103650 ] クロックソース:クロックソースarch_sys_counterに切り替えました [ 0.103810] VFS: ディスククォータ dquot_6.6.0 [ 0.103863] VFS: Dquotキャッシュハッシュテーブルエントリ数:512(次数0、4096バイト) [ 0.104030] pnp: pnP ACPI: 無効化 [ 0.110531] thermal_sys: 登録された熱制御器『step_wise』 [0.110535] thermal_sys:登録熱制御器「power_allocator」 [ 0.110837] NET: 登録プロトコルファミリ2 [ 0.111177] tcp_listen_portaddr_hash ハッシュテーブルエントリ数:2048(順序:3,32768バイト、線形) [ 0.111234] TCPはハッシュテーブルエントリを確立しました:32768(順序:6、262144バイト、線形) [ 0.111484] TCP バインドハッシュテーブルエントリ数:32768(順序:7、524288バイト、線形) [ 0.112031] TCP: ハッシュテーブルの設定(確立 32768 bind 32768) [ 0.112124] UDPハッシュテーブルエントリ数:2048(順序:4,65536バイト、線形) [ 0.112213] UDP-Lite ハッシュテーブルエントリ数:2048(順序:4,65536バイト、線形) [ 0.112402] NET: 登録プロトコルファミリ1 [ 0.112749] RPC: 登録済みのUNIXソケットトランスポートモジュール。 [ 0.112755] RPC: UDPトランスポートモジュールを登録しました。 [ 0.112761] RPC: TCPトランスポートモジュールを登録しました。 [ 0.112766] RPC: tcp NFSv4.1 バックチャネルトランスポートモジュールを登録しました。 [ 0.113143] PCI: CLS 0バイト、デフォルト64 [ 0.113846] ハードウェアパーフェインス:armv8_cortex_a53 PMUドライバで有効、7つのカウンターが利用可能 [ 0.114201] kvm [1]: IPAサイズ制限:40ビット [ 0.115382] KVM [1]: VGIC-v2@31020000 [ 0.115403] kvm [1]: GICシステムレジスタCPUインターフェースが有効 [ 0.115467] kvm [1]: VGIC 割り込み IRQ1 [ 0.115585] kvm [1]: Hypモードの初期化に成功 [ 0.118673] システムの信頼キーリングを初期化する [ 0.118773] ワーキングセット: timestamp_bits=44 max_order=20 bucket_order=0 [ 0.125681] スクワッシュフス:バージョン4.0(2009年1月31日) フィリップ・ラウガー [ 0.126353] NFS:id_resolver鍵タイプの登録 [ 0.126378 登録キータイプid_resolver [ 0.126383 登録キータイプid_legacy [ 0.126410] nfs4filelayout_init: NFSv4 ファイルレイアウトドライバ登録中... [ 0.126432] JFFS2: バージョン2.2。(NAND) © 2001-2006年 レッドハット社 [ 0.126818] 9p: v9fs 9p2000ファイルシステムサポートのインストール [ 0.142848] キータイプ非対称登録 [ 0.142855] 非対称キーパーサー 'x509' 登録済み [ 0.142887] ブロック層 SCSI ジェネリック(BSG)ドライバーバージョン0.4 ロード(メジャー244) [ 0.142894] IOスケジューラーMQ-期限登録済み [ 0.142899] IO スケジューラー カイバー登録済み [0.148268] EINJ:ACPIが無効化されました。 [ 0.156665] IMX-SDMA 302C0000.DMA-コントローラー:imx/sdma/sdma-imx7d.binの直接ファームウェアロードがエラー-2で失敗しました [ 0.156677] IMX-SDMA 302C0000.DMA-コントローラー:imx/sdma/sdma-imx7d.bin のsysfsフォールバックにフォールバックします [ 0.161815] mxs-dma 33000000.dma-apbh:初期化 [ 0.165552] バス周波数ドライバモジュールを読み込み完了 [ 0.165778] VPUおよびCPUの設定NOC [ 0.170146] シリアル:8250/16550 ドライバ、4ポート、IRQ共有有効 [ 0.172197] 30860000.serial:ttymxc0 (MMIO 0x30860000、irq = 31、base_baud = 1562500) は IMX です [ 1.136323] printk: コンソール [ttymxc0] が有効になりました [ 1.141150] 30890000.serial:ttymxc1 は MMIO 0x30890000(irq = 32、base_baud = 1562500)において IMX です [ 1.158703] IMX-DCSS 32E00000.display-controller:CTXLD:IRQ番号が出ません [ 1.165920] IMX-DCSS 32E00000.display-controller:サブモジュールの初期化失敗 [ 1.184064] ループ:モジュールロード完了 [ 1.189394] IMX AHCIドライバーが登録されています。 [ 1.196255] spi-nor spi3.0:n25q256a(32768 Kbytes) [ 1.206019] リブフィー:固定MDIOバス:プローブド [ 1.211027] tun: Universal TUN/TAPデバイスドライバ、1.6 [ 1.216789 thunder_xcv、バージョン 1.0 [ 1.220064 thunder_bgx、バージョン 1.0 [ 1.223330] NICPF、バージョン1.0 [ 1.226764] pps pps0: 新しいPPSソース ptp0 [ 1.236311] Freescale FMモジュール、FMD APIバージョン21.1.0 [ 1.241815] フリースケールFMポートモジュール [ 1.245492] fsl_mac: fsl_mac: FSL FMan MAC APIベースのドライバ [ 1.251227 ] fsl_dpa: FSL DPAA イーサネットドライバ [ 1.255718] fsl_advanced: FSL DPAA Advancedドライバ: [ 1.260697] fsl_proxy: FSL DPAAプロキシ初期化ドライバ [ 1.266378] fsl_oh: FSL FManオフライン解析ポートドライバ [ 1.272624] HCLGEが初期化中 [ 1.275952] hns3: Hisilicon Ethernet Network Driver for Hip08 ファミリ - バージョン [ 1.283182] hns3: 著作権 (c) 2017 Huawei Corporation。 [ 1.288551] e1000: Intel(R) PRO/1000 ネットワークドライバー - バージョン 7.3.21-k8-NAPI [ 1.295606] e1000: Copyright (c) 1999-2006 Intel Corporation. [ 1.301399] e1000e: Intel(R) PRO/1000 ネットワークドライバー - 3.2.6-k [ 1.307239] e1000e: Copyright(c) 1999 - 2015 Intel Corporation. [ 1.313209] igb: Intel(R) ギガビットイーサネットネットワークドライバー - バージョン 5.6.0-k [ 1.320180] igb: Copyright (c) 2007-2014 Intel Corporation. [ 1.325794] igbvf: Intel(R) ギガビット仮想機能ネットワークドライバー - バージョン 2.4.0-k [ 1.333636] igbvf: Copyright (c) 2009 - 2012 Intel Corporation. [ 1.339731] Sky2: ドライバーバージョン1.30 [ 1.344364] VFIO - ユーザーレベルのメタドライバーバージョン:0.3 [ 1.351924] ehci_hcd: USB 2.0 "強化"ホストコントローラ(EHCI)ドライバー [ 1.358469] EHCI-PCI:EHCI PCIプラットフォームドライバ [ 1.362958] EHCI-プラットフォーム:EHCI汎用プラットフォームドライバー [ 1.368368] ohci_hcd: USB 1.1 "オープン"ホストコントローラ(OHCI)ドライバー [ 1.374567] ohci-pci: OHCI PCIプラットフォームドライバー [ 1.379053] OHCI-プラットフォーム:OHCI汎用プラットフォームドライバー [ 1.384969] USBコア:登録済みの新しいインターフェースドライバーUAS [ 1.390332] USBコア:登録済みの新しいインターフェースドライバーUSBストレージ [ 1.396413] USBcore: 新しいインターフェースドライバーが登録usbserial_generic [ 1.402965] usbserial: 汎用として登録されたUSBシリアルサポート [ 1.409012] USBコア:登録済みの新しいインターフェースドライバー ftdi_sio [ 1.414786] usbserial: FTDI USB シリアルデバイスに登録されたUSBシリアルサポート [ 1.422131] USBcore: 登録済みの新しいインターフェースドライバー usb_serial_simple [ 1.428685] usbserial: carelinkに登録されたUSBシリアルサポート [ 1.434803] usbserial: zioに登録されたUSBシリアルサポート [ 1.440491] usbserial: Funsoftに登録されたUSBシリアルサポート [ 1.446524] usbserial: フラッシュローダー用USBシリアルサポート登録済み [ 1.452903] usbserial: Googleに登録されたUSBシリアルサポート [ 1.458847] usbserial: libtransistorに登録されたUSBシリアルサポート [ 1.465404] usbserial: vivopayに登録されたUSBシリアルサポート [ 1.471433] USBシリアル:USBシリアルサポート登録moto_modem [ 1.477727] usbserial: USBシリアルサポート登録済み motorola_tetra [ 1.484367] usbserial: USBシリアルサポート登録済み novatel_gps [ 1.490744] usbserial: hp4xに登録されたUSBシリアルサポート [ 1.496518] usbserial: suuntoに登録されたUSBシリアルサポート [ 1.502468] usbserial: USBシリアルサポート登録済み siemens_mpi [ 1.508863] USBCORE: 登録済みの新しいインターフェースドライバー usb_ehset_test [ 1.517801] 入力: 30370000.snvs:SNVS-PowerKeyas: /devices/platform/soc@0/soc@0:bus@30000000/30370000.SNVS/30370000.SNVS :snvs-powerkey/input/input0 [ 1.532948] snvs_rtc 30370000.snvs:snvs-rtc-lp:RTC0として登録 [ 1.539232] i2c /dev エントリードライバー [ 1.543333] MX6S-CSI 30a90000.csi1_bridge:初期化中 [ 1.551157] imx2-wdt 30280000.watchdog:タイムアウト 60秒(Nowayout=0) [ 1.557726] Bluetooth: HCI UARTドライバ バージョン2.3 [ 1.562182 Bluetooth: HCI UARTプロトコルH4が登録済み [ 1.567332] Bluetooth: HCI UARTプロトコル BCSP登録済み [ 1.572675] Bluetooth: HCI UARTプロトコルLL登録済み [ 1.577823] Bluetooth: HCI UARTプロトコルATH3K登録済み [ 1.583254] Bluetooth: HCI UARTプロトコル 3線式(H5)登録済み [ 1.589615] Bluetooth: HCI UARTプロトコル Broadcom登録 [ 1.595303] Bluetooth: HCI UARTプロトコルQCA登録済み [ 1.602819] sdhci:セキュアデジタルホストコントローラ インターフェース ドライバ [ 1.609009] sdhci: Copyright(c) ピエール・オスマン [ 1.613563] Synopsys Designware マルチメディアカード インターフェース ドライバ [ 1.620207] sdhci-pltfm:SDHCI プラットフォーム およびOFドライバヘルパー [ 1.628408] ledtrig-cpu: CPU上の活動を示すために登録されました [ 1.635591] CAAM 3090000.crypto:デバイスID = 0x0a16040100000000 (Era 9) [ 1.642309] caam 30900000.crypto:ジョブリング = 2、qi = 0 [ 1.663346] caam アルゴリズムが /proc/crypto に登録されました [ 1.669415] caam 30900000.crypto:caam pkc アルゴリズムが /proc/crypto に登録されています [ 1.676833] caam 30900000.crypto:rng-caamを登録しています [ 1.682734] デバイス caam-keygen が登録されました [ 1.688412] caam-snvs 30370000.caam-snvs:違反ハンドラーは武装 - 非安全状態 [ 1.696951] USBcore: 登録済みの新しいインターフェース ドライバー usbhid [ 1.702537] usbhid: USB HIDコアドライバー [ 1.708238] FSL,qmanノードはありません [ 1.711121] Freescale USDPAAプロセスドライバー [ 1.715333] FSL-USDPAA:地域は見つかりません [ 1.719175] Freescale USDPAAプロセスIRQドライバー [ 1.727359] 受験者:DTからの導管法のプロービング。 [ 1.732535] optee: リビジョン3.10 (A991C904) [ 1.733805] OPEE:動的共有メモリが有効です [ 1.743259] optee: 初期化されたドライバー [ 1.744339] ランダム:速いイニット完了 [ 1.750916] wm8524-codec オーディオ-codec: ミュートラインを取得できず -517 [ 1.765846] IMX-SPDIF sound-spdif: ASoC: リンク初init 失敗 S/PDIF PCM: -517 [ 1.769126] ランダム:CRNG init完了 [ 1.773046] IMX-SPDIF Sound-HDMI-ARC: ASoC: リンク初init 失敗 S/PDIF PCM: -517 [ 1.784368] IMX-AK4458 Sound-AK4458: SAIプラットフォーム装置を発見できません [ 1.791003] IMX-AK4458: 音のプローブがエラー-22で失敗 [ 1.797515] IMX-AK5558 Sound-AK5558: SAIプラットフォーム装置を発見できません [ 1.804150] IMX-AK5558: サウンド-AK5558のプローブがエラー-22で失敗 [ 1.811049] IMX-CDNHDMI Sound-HDMI: ASoC: init not not link imx8 hdmi: -517 [ 1.818203] IMX-CDNHDMI サウンド-HDMI: snd_soc_register_card 失敗 (-517) [ 1.825193] pktgen:パケット性能テスト用のパケットジェネレーター。バージョン:2.75 [ 1.842927] NET: 登録プロトコルファミリ26 [ 1.848054] NET: 登録プロトコルファミリ10 [ 1.853151] IPv6によるセグメントルーティング [ 1.856913] NET: 登録プロトコルファミリ17 [ 1.861955] Bluetooth: RFCOMM TTYレイヤーの初期化 [ 1.866851] Bluetooth:RFCOMMソケット層の初期化 [ 1.872040] Bluetooth: RFCOMM バージョン 1.11 [ 1.875812] Bluetooth: BNEP(イーサネットエミュレーション) バージョン1.3 [ 1.881147] Bluetooth: BNEPフィルター: プロトコルマルチキャスト [ 1.886385] Bluetooth:BNEPソケット層の初期化 [ 1.891358] Bluetooth: HIDP(ヒューマンインターフェースエミュレーション) バージョン1.2 [ 1.897302] Bluetooth:HIDPソケット層が初期化済み [ 1.902310] 8021q: 802.1Q VLAN サポート v1.8 [ 1.906528] lib80211:IEEE802.11ドライバの共通ルーチン [ 1.912316] 9pnet: 9P2000サポートのインストール [ 1.916627] TSN 汎用ネットリンクモジュール v1 init... [ 1.921424] キータイプ 登録dns_resolver [ 1.927101] 登録済みタスク統計 バージョン1 [ 1.931227] コンパイルされたX.509証明書の読み込み [ 1.962841] ov5640_mipi 0-003c: センサーリセットピンなし [ 1.968635] ov5640_mipi 0-003c: 0-003c 供給DOVDDは見つかりません、ダミーレギュレーター使用中 [ 1.976440] ov5640_mipi 0-003c: 0-003c 供給DVDDはダミーレギュレーター使用で見つかりません [ 1.984143] ov5640_mipi 0-003c: 0-003c 電源AVDDは見つかりません、ダミーレギュレーター使用中 [ 2.005016] ov5640_mipi 0-003c: レジグエラーを読み取る: reg=300a [ 2.010347] ov5640_mipi 0-003c: カメラが見つかりません [ 2.016834] pfuze100-regulator 0-0008: 全層:2、金属層:1 [ 2.023823] pfuze100-レギュレーター 0-0008: FAB: 0, FIN: 0 [ 2.028903] pfuze100-regulator 0-0008: pfuze100 発見。 [ 2.062317] i2c i2c-0:IMX I2Cアダプター登録済み [ 2.068362] ov5640_mipi 1-003c: センサーリセットピンなし [ 2.074153] ov5640_mipi 1-003c: 1-003c 供給DOVDDは見つからず、ダミーレギュレーター使用中 [ 2.081963] ov5640_mipi 1-003c: ダミーレギュレーター使用で1-003cの供給DVD(見つからない) [ 2.089673] ov5640_mipi 1-003c: ダミーレギュレーター使用で1-003c電源AVDDが見つかりません [ 2.107955] ov5640_mipi 1-003c: レジグエラーを読み取る: reg=300a [ 2.113285] ov5640_mipi 1-003c: カメラは見つかりません [ 2.118327] i2c i2C-1: IMX I2Cアダプタ登録済み [ 2.124341] ak4458 2-0010: ダミーレギュレーター使用中、2-0010 供給DVD(見つからない) [ 2.131623] ak4458 2-0010: ダミーレギュレーター使用中、2-0010 供給AVDDが見つかりません [ 2.139766] ak4458 2-0012: ダミーレギュレーター使用中、2-0012 供給DVD(見つかりません) [ 2.147080] ak4458 2-0012: 2-0012 供給AVDDは見つかりません、ダミーレギュレーター使用中 [ 2.155213 ak5558 2-0013: ダミーレギュレーター使用中、2-0013 供給DVD(見つからない) [ 2.162491] ak5558 2-0013: 2-0013 ダミーレギュレーター使用中、供給AVDDが見つかりません [ 2.170592 ak4458 2-0011: ダミーレギュレーター使用中、2-0011 供給DVDが見つからず [ 2.177870] ak4458 2-0011: 2-0011 供給AVDDが見つからず、ダミーレギュレーターを使用 [ 2.185735] i2c i2c-2: IMX I2Cアダプター登録 [ 2.190954] IMX8MQ-USB-PHY 381F0040.USB-PH:381f0040.usb-phy電源Vbusが見つかりません。ダミーレギュレータを使用します。 [ 2.200902] imx8mq-usb-phy 382f0040.usb-phy:382f0040.usb-phyダミーレギュレーター使用中の供給VBUSが見つかりません [ 2.217320] [drm] vblankタイムスタンプキャッシュRev 2(2013年10月21日)をサポートしています。 [ 2.223952] [drm] vblankタイムスタンプクエリのドライバーサポートはありません。 [ 2.232404] cdns-mhdp-imx 32c00000.hdmi:レーンマッピング0xe4 [ 2.242324] IMX-DCSS 32E00000.display-controller:バウンド32C00000.HDMI(OPS cdns_mhdp_imx_ops) [ 2.2522222] [drm] 32e0000.display-controller 用に imx-dcss 1.0.0 20190917 を初期化しましたマイナー0について [ 2.288635] cdns-mhdp-imx 32c00000.hdmi:0,ff,ff,ff,ff,ff,ff,0 [ 2.329025] cdns-mhdp-imx 32c00000.hdmi:0,ff,ff,ff,ff,ff,ff,0 [ 2.329856] [drm] モード: 1920x1080p148500 [ 2.355662] [drm] ピクセルクロック: 148500 KHz、文字クロック: 148500、bpc は 8 ビットです。 [ 2.355666] [drm] VCO周波数は5940000 KHz [ 2.469363] [drm] Sink Not サポート SCDC [ 2.470592 [DRM] ベンダーインフォフレームなし [ 2.567286] コンソール:カラーフレームバッファデバイス240x67への切り替え [ 2.634396] IMX-DCSS 32E00000.display-controller:FB0: IMX-DCSSDRMFB フレームバッファデバイス [ 2.644774] pps pps0: 新しいPPSソース ptp0 [ 2.654599] FEC 30BE0000.イーサネット:無効MACアドレス:00:00:00:00:00:00 [ 2.661419] FEC 30BE0000.イーサネット:ランダムMACアドレスの使用:7a:a8:f7:ad:6f:de [ 2.669747] libphy: fec_enet_mii_bus: 探査 [ 2.678881] FEC 30BE0000.イーサネット eth0: 登録済みPHCデバイス0 [ 2.685802] OF: グラフ:/soc@0/usb-phy@381f0040 にポートノードが見つかりません [ 2.693208] XHCi-HCD.1.auto:xHCIホストコントローラ [ 2.698722] XHCI-HCD、XHCI-HCD.1.auto:新しいUSBバスが登録され、バス番号1が割り当てられました [ 2.706515] xhci-hcd xhci-hcd.1.auto:HCCパラメータ0x0220fe6c HCIバージョン0x110クイーク0x0000000001010010 [ 2.715968] XHCI-HCD、XHCI-HCD.1.オート:irq 51、io mem 0x38200000 [ 2.723624] ハブ 1-0:1.0:USBハブが見つかった [ 2.727413] ハブ 1-0:1.0:ポート1つ検出 [ 2.731621] XHCi-HCD.1.auto:xHCIホストコントローラ [ 2.737136] XHCi-HCD XHCI-HCD.1.auto:新しいUSBバスが登録され、バス番号2が割り当てられました [ 2.744828] XHCi-HCD、XHCI-HCD.1.auto:ホストはUSB 3.0 SuperSpeedに対応しています [ 2.751424] USB USB2: このホストのLPMアルゴリズムは不明で、LPMは無効化されます。 [ 2.760494] ハブ 2-0:1.0:USBハブが見つかった [ 2.764276] ハブ 2-0:1.0:ポート1つ検出 [ 2.769327] IMX-CPUFREQ-DT IMX-CPUFREQ-DT: CPU 速度グレード3 MKT セグメント0サポート-ハードウェア0x8 0x1 [ 2.804575] mmc0: 30b40000.mmc 上のSDHCIコントローラ [30b40000.mmc]ADMAを使用する [ 2.812632] sdhci-esdhc-imx 30b50000.mmc:CD GPIOを入手しました [ 2.849456 ] mmc1: SDHCIコントローラを30b50000.mmc [30b50000.mmc]ADMAを使用する [ 2.859349] galcore: clk_get 2d コアクロックに失敗しました。2d/vg を無効にします。 [ 2.865785] Galcore バージョン 6.4.3.p1.305572 [ 2.923095] mmc0: アドレス0001に新しいHS400 MMCカードが接続されました [ 2.943854] mmcblk0: mmc0:0001 R1J56L 13.8 GiB [ 2.948554] mmcblk0boot0: mmc0:0001 R1J56L パーティション 1 4.00 MiB [ 2.967471] mmcblk0boot1: mmc0:0001 R1J56L パーティション 2 4.00 MiB [ 2.974145] mmcblk0rpmb: mmc0:0001 R1J56L パーティション 3 128 KiB、chardev (237:0) [ 3.005044] [drm] マイナー 1 で 38000000.gpu3d 用に vivante 1.0.0 20170808 を初期化しました [ 3.018328] hantrodec: モジュールが挿入されました。メジャー=236 [ 3.026226] MMC1: ホストは読み取り専用スイッチをサポートしません(書き込み有効を前提とします) [ 3.035961] debugfs: Directory '308b0000.sai'親「WM8524-オーディオ」はすでに存在しています! [ 3.044243] asoc-simple-card sound-wm8524: wm8524-hifi <-> 308b0000.sai マッピングOK [ 3.051890] asoc-simple-card sound-wm8524: ASoC: DMI ベンダー名がありません! [ 3.059971] imx-spdif sound-spdif: ASoC: リンク S/PDIF PCM の初期化に失敗しました: -517 [ 3.067574] imx-spdif sound-hdmi-arc: ASoC: リンク S/PDIF PCM の初期化に失敗しました: -517 [ 3.067660] usb 1-1: xhci-hcd を使用した新しい高速 USB デバイス番号 2 [ 3.075586] debugfs: ディレクトリ '30050000.sai'親の『IMX-オーディオ-HDMI』はすでに存在します! [ 3.089979] imx-cdnhdmi sound-hdmi: i2s-hifi <-> 30050000.sai マッピングは正常です [ 3.096720] imx-cdnhdmi sound-hdmi: ASoC: DMI ベンダー名がありません! [ 3.102524] debugfs: ディレクトリ 'dapm' 内のファイル 'Capture' は既に存在します! [ 3.110579] 入力:imx-オーディオ-hdmi HDMI ジャック /devices/プラットフォーム/sound-hdmi/sound/card1/input1 [ 3.120604] IMX8MQ-pinCtrl 30330000.iomuxc:PIN MX8MQ_IOMUXC_NAND_CE2_BはすでにPTN36043から要請されています。請求できません 0-0050 [ 3.132021] IMX8MQ-pinCtrl 30330000.iomuxc:pin-64 (0-0050) ステータス -22 [ 3.138562] imx8mq-pinctrl 30330000.iomuxc:DのグループTypeCGRPからピン64(MX8MQ_IOMUXC_NAND_CE2_B)をリクエストできませんでした EVICE 30330000.iomuxc [ 3.151272] tcpci 0-0050: 設定の適用エラー、元に戻します [ 3.157736] tcpci: 0-0050 のプローブがエラー -22 で失敗しました [ 3.164065] imx-spdif sound-spdif: ASoC: リンク S/PDIF PCM の初期化に失敗しました: -517 [ 3.171575] imx-spdif sound-hdmi-arc: ASoC: S/PDIF PCM リンクの初期化に失敗しました: -517 [ 3.180284] imx-spdif sound-spdif: ASoC: リンク S/PDIF PCM の初期化に失敗しました: -517 [ 3.187765] imx-spdif sound-hdmi-arc: ASoC: リンク S/PDIF PCM の初期化に失敗しました: -517 [ 3.197873] snvs_rtc 30370000.snvs:snvs-rtc-lp:システムクロックを1970-01-01T00:00:01 UTC(1)に設定 [ 3.202384 ] MMC1:アドレス aaaa に新しい超高速SDR104 SDHCカード [ 3.207164] cfg80211: 規制データベース用のコンパイルされたX.509証明書の読み込み [ 3.214314] mmcblk1: mmc1:aaaa SC16G 14.8 GiB [ 3.225796] cfg80211: loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7' [ 3.230978] MMCBLK1: P1 P2 [ 3.232407] プラットフォーム regulatory.0:regulatory.dbの直接ファームウェアロードはエラー-2で失敗しました。 [ 3.237215] IMX-SPDIF Sound-spdif: ASoC: Failed to init link S/PDIF PCM: -517 [ 3.244370] ALSAデバイスリスト: [ 3.251320] IMX-SPDIF Sound-HDMI-ARC: ASoC: リンク初init 失敗 S/PDIF PCM: -517 [ 3.253894] プラットフォーム規制.0:regulatory.db の sysfs フォールバックにフォールバックします [ 3.255659] #0: WM8524-オーディオ [ 3.255661] #1: IMX-オーディオ-HDMI [ 3.329094 ハブ 1-1:1.0:USBハブが見つかりました [ 3.333920] ハブ 1-1:1.0: 4つのポートが検出されました [ 3.396558] imx-spdif sound-spdif: ASoC: リンク S/PDIF PCM の初期化に失敗しました: -517 [ 3.404236] imx-spdif sound-hdmi-arc: ASoC: S/PDIF PCM リンクの初期化に失敗しました: -517 [ 3.591627] EXT4-fs (mmcblk1p2): リカバリ完了 [ 3.597050] EXT4-fs (mmcblk1p2): 順序付きデータモードでファイルシステムをマウントしました。オプション: (null) [ 3.605372] VFS: デバイス 179:98 にルート (ext4 ファイルシステム) をマウントしました。 [ 3.619633] devtmpfs: マウント済み [ 3.623395] 未使用のカーネルメモリを解放中: 2880K [ 3.627992] /sbin/init を init プロセスとして実行 [ 3.763123] systemd[1]: システム時刻がビルド時刻より前なので、クロックを進めます。 [ 3.786018] systemd[1]: systemd 243.2+ がシステムモードで実行されています。(+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UT MP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid) [ 3.807965] systemd[1]: アーキテクチャ arm64 を検出しました。 NXP i.MX リリース ディストリビューション 5.4-zeus (zeus) へようこそ! [ 3.863773] systemd[1]: ホスト名を に設定しました。 [ 4.060742] systemd[1]: /lib/systemd/system/dbus.socket:5: ListenStream= はレガシーディレクトリ /var/r より下のパスを参照しています un/、/var/run/dbus/system_bus_socket を /run/dbus/system_bus_socket に更新しています。ユニットファイルを適切に更新してください。 [ 4.091722] systemd[1]: /lib/systemd/system/syslogd.service:8:PIDFile= は、レガシーディレクトリ /var/ru より下のパスを参照します。 n/、/var/run/syslogd.pid を更新中 → /run/syslogd.pid;ユニットファイルを適切に更新してください。 [ 4.122304] systemd[1]: /lib/systemd/system/rpcbind.socket:5:ListenStream= は、レガシーディレクトリ /va より下のパスを参照します。 r/run/、/var/run/rpcbind.sock を更新中 → /run/rpcbind.sock;ユニットファイルを適切に更新してください。 [ 4.148416] systemd[1]: /lib/systemd/system/klogd.service:8: PIDFile= はレガシーディレクトリ /var/run/ より下のパスを参照しています 、/var/run/klogd.pid を /run/klogd.pid に更新します。ユニットファイルを適切に更新してください。 [ 4.265358] systemd[1]: system-getty.slice:ユニットはIPファイアウォールを設定していますが、ローカルシステムはBPF/cgをサポートしていません ROUPファイアウォール。 [ 4.277777] systemd[1]: (この警告は、IPファイアウォールを使用する最初のユニットに対してのみ表示されます。) [ 4.288085] systemd[1]: スライス system-getty.slice を作成しました。 [ OK ] スライス system-getty.slice を作成しました。 [ OK ] スライス system-serial\x2dgetty.slice を作成しました。 [ OK ]Created slice ユーザー and Session Slice。 [ OK ] コンソールディレクトリ監視へのパスワード ��…ts のディスパッチを開始しました。 [ OK ] パスワード要求をウォールディレクトリ監視に転送する処理を開始しました。 [ OK ] ホストおよびネットワーク名ルックアップのターゲットに到達しました。 [ OK ] ターゲット Paths に到達しました。 [ OK ] リモートファイルシステムのターゲットに到達しました。 [ OK ] 目標のスライス数に達しました。 [ OK ] ターゲットのスワップに到達しました。 [ OK ] Syslogソケットで待機しています。 [ OK ] initctl 互換性名前付きパイプでリッスンしています。 [ OK ] ジャーナル監査ソケットでリッスンしています。 [ OK ] ジャーナルソケット (/dev/log) でリッスンしています。 [ OK ] ジャーナルソケットでリッスンしています。 [ OK ] ネットワークサービス Netlink ソケットで待機しています。 [ OK ] udev コントロールソケットで待機しています。 [ OK ] udev カーネル ソケットでリッスンしています。 巨大ページファイルシステムをマウントしています... POSIXメッセージキューファイルシステムをマウントしています... カーネルデバッグファイルシステムをマウントしています... 一時ディレクトリ(/tmp)をマウントしています... 現在のカーネル用のst��…odeリストの作成を開始します... ジャーナルサービスを開始します... カーネル設定ファイルシステムをマウントしています... ルートファイルシステムとカーネルファイルシステムの再マウントを開始しています... カーネル変数の適用を開始します... udev コールドプラグを全デバイスに向けて起動しています... 仮想コンソールのセットアップを開始しています... [OK] ジャーナルサービスを開始しました。 [失敗] 巨大ページファイルシステムのマウントに失敗しました。 詳細は「systemctl status dev-hugepages.mount」を参照してください。 [失敗] POSIX メッセージキューファイルシステムのマウントに失敗しました。 詳細は「systemctl status dev-mqueue.mount」を参照してください。 [失敗] カーネルデバッグファイルシステムのマウントに失敗しました。 「systemctl status sys-kernel-debug.mount」を参照してください。詳細は [失敗] 一時ディレクトリ (/tmp) のマウントに失敗しました。 詳細は「systemctl status tmp.mount」を参照してください。 [依存関係] ログインサービスの依存関係が満たされませんでした。 [依存関係] ネットワーク時刻同期の依存関係が失敗しました。 [ OK ] 現在のカーネルのsta��…ノードのリストの作成を開始しました。 [失敗] カーネル構成ファイルシステムのマウントに失敗しました。 詳細については、「systemctl status sys-kernel-config.mount」を参照してください。 [失敗] ルートファイルシステムとカーネルファイルシステムの再マウントを開始できませんでした。 「systemctl status systemd-remount-fs.service」を参照してください。詳細は [OK] カーネル変数の適用を開始しました。 [OK] 仮想コンソールのセットアップを開始しました。 [OK] 目標のシステム時刻設定に到達しました。 [OK] システム時刻同期の目標に到達しました。 ジャーナルを永続ストレージにフラッシュしています... [ 5.138178] systemd-journald[250]: ランタイムジャーナルをフラッシュするためのクライアント要求を受信しました。 /dev に静的デバイスノードの作成を開始しています... [ OK ] ジャーナルを永続ストレージにフラッシュする処理を開始しました。 [ OK ] /dev に静的デバイスノードの作成を開始しました。 [ OK ] ターゲット Local File Systems (Pre) に到達しました。 /var/volatile... udevカーネルデバイスマネージャーを起動中... [ OK ]すべてのデバイスをUdevでコールドプラグしました。 [失敗] /var/volatile のマウントに失敗しました。 「systemctl status var-volatile.mount」を参照してください。詳細は [DEPEND] バインドマウント揮発性 /srv の依存関係が失敗しました。 [DEPEND] バインドマウント揮発性 /var/cache の依存関係が失敗しました。 [DEPEND] バインドマウント揮発性 /var/spool の依存関係が失敗しました。 [DEPEND] Bind mount volatile /var/lib の依存関係が失敗しました。 [DEPEND] ローカルファイルシステムの依存関係が失敗しました。 [ OK ]udevカーネルデバイスマネージャーを起動しました。 [ OK ] ディスパッチパスワード ��…ts をコンソールディレクトリ監視に停止しました。 [ OK ] ウォールディレクトリ監視へのパスワードリクエストの転送を停止しました。 [OK] 目標のタイマーに到達しました。 [ OK ] ターゲットネットワーク (Pre) に到達しました。 起動画面(Psplash Boot Screen)を開始しています... [ OK ] ログインプロンプトのターゲットに到達しました。 [ OK ] Syslogソケットを閉じました。 ネットワークサービスを開始しています... ロード/セーブ時のランダムシードを開始します... [ OK ] ターゲット Sockets に到達しました。 [OK] 緊急シェルを開始しました。 [OK] 緊急モードに到達しました。 揮発性ファイルとディレクトリの作成を開始します... [OK] ネットワークサービスを開始しました。 [OK] 起動スプラッシュ画面を開始しました。 [ OK ] ランダムシードのロード/保存を開始しました。 [OK] 揮発性ファイルとディレクトリの作成を開始しました。 [ OK ] スライス system-weston.slice を作成しました。 [ OK ] コンソールディレクトリ監視へのパスワード ��…ts のディスパッチを開始しました。 [ OK ]停止した目標 Emerg[5.777831] imx-sdma 30bd0000.dma-controller:ファームウェア4.5をロードしました エンシーモード。 [OK] ターゲットネットワークに到達しました。 [OK] サウンドカードのターゲットに到達しました。 巨大なページファイルのマウント... [ 5.841878] Atheros 8031 イーサネット 30be0000.ethernet-1:00:接続されたPHYドライバー [Atheros 8031イーサネット] (mii_bus:phy_addr= 30be0000.ethernet-1:00,irq=POLL) POSIXメッセージキューファイルシステムをマウントしています... カーネルデバッグファイルシステムをマウントしています... 一時ディレクトリ(/tmp)をマウントしています... /var/volatile をマウントしています... カーネル設定ファイルシステムをマウントしています... ルートファイルシステムとカーネルファイルシステムの再マウントを開始しています... [OK] 緊急砲弾を停止しました。 [失敗] 巨大ページファイルシステムのマウントに失敗しました。 詳細については、「systemctl status dev-hugepages.mount」を参照してください。 [失敗] POSIX メッセージキューファイルシステムのマウントに失敗しました。 詳細は「systemctl status dev-mqueue.mount」を参照してください。 [失敗] カーネルデバッグファイルシステムのマウントに失敗しました。 「systemctl status sys-kernel-debug.mount」を参照してください。詳細は [失敗] 一時ディレクトリ (/tmp) のマウントに失敗しました。 詳細は「systemctl status tmp.mount」を参照してください。 [依存関係] ネットワーク時刻同期の依存関係が失敗しました。 [失敗] /var/volatile のマウントに失敗しました。 「systemctl status var-volatile.mount」を参照してください。詳細は [DEPEND] バインドマウント揮発性 /srv の依存関係が失敗しました。 [DEPEND] バインドマウント揮発性 /var/cache の依存関係が失敗しました。 [DEPEND] バインドマウント揮発性 /var/spool の依存関係が失敗しました。 [DEPEND] Bind mount volatile /var/lib の依存関係が失敗しました。 [DEPEND] ローカルファイルシステムの依存関係が失敗しました。 [失敗] カーネル構成ファイルシステムのマウントに失敗しました。 詳細については、「systemctl status sys-kernel-config.mount」を参照してください。 [失敗] ルートファイルシステムとカーネルファイルシステムの再マウントを開始できませんでした。 「systemctl status systemd-remount-fs.service」を参照してください。詳細は [ OK ] system-systemd\x2dfsck.slice というスライスを作成しました。 [ OK ] ディスパッチパスワード ��…ts をコンソールディレクトリ監視に停止しました。 /dev/mmcblk1p1 のファイルシステムチェックを開始しています... [OK] 緊急シェルを開始しました。 [OK] 緊急モードに到達しました。 システム起動/シャットダウンに関するUTMPアップデートを開始します... [ OK ] システム起動/シャットダウンに関するUTMPアップデートを開始しました。 システムランレベル変更に関するUTMPアップデートを開始します... [ OK ] システムランレベル変更に関するUTMPの更新を開始しました。 [ OK ] /dev/mmcblk1p1 のファイルシステムチェックを開始しました。 /run/media/mmcblk1p1のマウント中... [不合格]/run/media/mmcblk1p1のマウントに失敗しました。 詳細は「systemctl status run-media-mmcblk1p1.mount」を参照してください。 あなたは緊急事態モードに入っています。ログイン後、「journalctl -xb」と入力して表示します。 システムログ、再起動するには「systemctl reboot」、または「systemctl default」もしくは「exit」 起動するには、メンテナンスのためにEnterキーを押してください (またはCtrl+Dを押して続行): sh-5.0# スーパーユーザー権限が機能していないようです。 敬具 i.MX 8ファミリ | i.MX 8QuadMax (8QM) | 8QuadPlus Linux Yocto Project Re: imx8mq yocto zeus err. 「仮想通貨復旧サービス」と聞くと、疑念を抱くのは当然です。残念ながら、すでに仮想通貨を失ってしまった人々は、しばしば二度目の復旧詐欺の標的にされてしまいます。 TECHY FORCE CYBER RETRIVALでは、まず「約束の前に証拠を示す」という原則から始めます。 私たちの働き方 まず、損失の状況を確認し、取引ハッシュ、ウォレットアドレス、ブロックチェーンの詳細、スクリーンショット、事故に関連する通信などの関連情報を収集します。 次に、入手可能なブロックチェーンの活動を分析し、資金がどのように移動したかを把握し、資金回収や報告の手順を確立するのに役立つ可能性のある情報を特定します。 また、各CASEの制約も説明します。正当な回収業者は盗まれた暗号通貨の回収を保証することはできません。なぜなら、結果は資産の移動先、追跡可能かどうか、利用可能な法的または技術的手段などの要因に依存しているからです。 回収詐欺から身を守る 信頼できる復旧サービスは、秘密鍵、シードフレーズ、パスワード、認証コードを開示するよう強要すべきではありません。「解除」「税金」「解放」手数料の緊急ペイメントを要求しながら、資金が返金されると保証する人には注意してください。 回収サービスに料金を支払う前に、会社を確認し、料金やサービスを書面で理解し、元の損失に関するすべての証拠を保管してください。 TECHY FORCE CYBER RETRIEVALは、ブロックチェーン分析、デジタル証拠のレビュー、詐欺調査、および現実的な復旧評価に重点を置いています。 回復が可能であれば、その証拠は正当な前進の道筋を示すのに役立つはずだ。そうでないなら、あなたは正直な評価を受ける権利があります。空約束を繰り返す必要はありません。 Re: imx8mq yocto zeus err. ご回答ありがとうございます。 YOCTOビルドプロセス中にエラーが発生したようです。 Zeusのすべてのバージョンを削除し、リポジトリフェーズで最初からやり直して、正常な起動を確認しました。 よろしくお願いします。 Re: imx8mq yocto zeus err. こんにちは、kangmw086さん ログから:「/run/media/mmcblk1p1のマウントに失敗しました」問題があるようです カーネルの起動パラメータでSDポートを使うと、 表54。Linux uSDHCの関係性 i.MX Linuxユーザーガイド よろしくお願いします イゴール
View full article
help:P2020RDB SCH I need this CPU SCH file for study,can somebody send me this PDF or SCH file  THANKS!! QorIQ P2 Devices Re: help:P2020RDB SCH  I'd be happy to help you find information, resources, or documentation for your studies. Re: help:P1020RDB SCH pcb bom can  you  offer  to  give  those  file? thanks Re: help:P2020RDB SCH See attached file. Have a great day, Pavel Chubakov ----------------------------------------------------------------------------------------------------------------------- Note: If this post answers your question, please click the Correct Answer button. Thank you! -----------------------------------------------------------------------------------------------------------------------
View full article
[S32DS] eclipse - java.io.FileNotFoundException !? C:\ 目录下没有名为 `git` 的文件夹。 我的 `git-for-windows.ico`文件位于 D:\msys64\mingw64\share\git\git-for-windows.ico 每次我编译东西的时候,它都会弹出来。 真烦人。 CY9_0-1787121511238.pngCY9_0-1787121511238.pngCY9_0-1787121511238.pngCY9_0-1787121511238.png -- org.eclipse.e4.core.di.InjectionException: org.eclipse.swt.SWTException: i/o error (java.io.FileNotFoundException: C:\Git\mingw64\share\git\git-for-windows.ico (系统找不到指定的路径。)) 在 org.eclipse.e4.core.internal.di.MethodRequestor.execute(MethodRequestor.java:68) 在 org.eclipse.swt.widgets.Synchronizer.syncExec(Synchronizer.java:236) 在 org.eclipse.ui.internal.UISynchronizer.syncExec(UISynchronizer.java:133) 在 org.eclipse.swt.widgets.Display.syncExec(Display.java:4742) 在 org.eclipse.e4.ui.workbench.swt.DisplayUISynchronize.syncExec(DisplayUISynchronize.java:34) 在 org.eclipse.e4.ui.internal.di.UIEventObjectSupplier$UIEventHandler.handleEvent(UIEventObjectSupplier.java:64) 在 org.eclipse.equinox.internal.event.EventHandlerWrapper.handleEvent(EventHandlerWrapper.java:205) 在 org.eclipse.equinox.internal.event.EventHandlerTracker.dispatchEvent(EventHandlerTracker.java:203) 在 org.eclipse.equinox.internal.event.EventHandlerTracker.dispatchEvent(EventHandlerTracker.java:1) 在 org.eclipse.osgi.framework.eventmgr.EventManager.dispatchEvent(EventManager.java:234) 在 org.eclipse.osgi.framework.eventmgr.ListenerQueue.dispatchEventSynchronous(ListenerQueue.java:151) 在 org.eclipse.equinox.internal.event.EventAdminImpl.dispatchEvent(EventAdminImpl.java:133) 在 org.eclipse.equinox.internal.event.EventAdminImpl.sendEvent(EventAdminImpl.java:75) 在 org.eclipse.equinox.internal.event.EventComponent.sendEvent(EventComponent.java:44) 在 org.eclipse.e4.ui.services.internal.events.EventBroker.send(EventBroker.java:55) 在 org.eclipse.e4.ui.internal.workbench.UIEventPublisher.notifyChanged(UIEventPublisher.java:63) 在 org.eclipse.emf.common.notify.impl.BasicNotifierImpl.eNotify(BasicNotifierImpl.java:424) 在 org.eclipse.e4.ui.model.application.ui.impl.UIElementImpl.setVisible(UIElementImpl.java:361) 在 org.eclipse.e4.ui.workbench.renderers.swt.ContributionRecord.updateVisibility(ContributionRecord.java:113) 在 org.eclipse.e4.ui.workbench.renderers.swt.MenuManagerRendererFilter.updateElementVisibility(MenuManagerRendererFilter.java:191) 在 org.eclipse.e4.ui.workbench.renderers.swt.MenuManagerRendererFilter.updateElementVisibility(MenuManagerRendererFilter.java:202) 在 org.eclipse.e4.ui.workbench.renderers.swt.MenuManagerShowProcessor.showMenu(MenuManagerShowProcessor.java:256) 在 org.eclipse.e4.ui.workbench.renderers.swt.MenuManagerShowProcessor.menuAboutToHide(MenuManagerShowProcessor.java:114) 在 org.eclipse.jface.internal.MenuManagerEventHelper.showEventPostHelper(MenuManagerEventHelper.java:95) 在 org.eclipse.jface.action.MenuManager.handleAboutToShow(MenuManager.java:469) 在 org.eclipse.jface.action.MenuManager.access$1(MenuManager.java:463) 在 org.eclipse.jface.action.MenuManager$2.menuShown(MenuManager.java:495) 在 org.eclipse.swt.widgets.TypedListener.handleEvent(TypedListener.java:259) 在 org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:89) 在 org.eclipse.swt.widgets.Display.sendEvent(Display.java:4209) 在 org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1043) 在 org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1067) 在 org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1048) 在 org.eclipse.swt.widgets.Control.WM_INITMENUPOPUP(Control.java:5157) 在 org.eclipse.swt.widgets.Control.windowProc(Control.java:4789) 在 org.eclipse.swt.widgets.Canvas.windowProc(Canvas.java:340) 在 org.eclipse.swt.widgets.Decorations.windowProc(Decorations.java:1480) 在 org.eclipse.swt.widgets.Shell.windowProc(Shell.java:2263) 在 org.eclipse.swt.widgets.Display.windowProc(Display.java:4930) 在 org.eclipse.swt.internal.win32.OS.TrackPopupMenu(本地方法) 在 org.eclipse.swt.widgets.Menu._setVisible(Menu.java:237) 在 org.eclipse.swt.widgets.Display.runPopups(Display.java:4067) 在 org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3620) 在 org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine$5.run(PartRenderingEngine.java:1157) 在 org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:338) 在 org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.run(PartRenderingEngine.java:1046) 在 org.eclipse.e4.ui.internal.workbench.E4Workbench.createAndRunUI(E4Workbench.java:155) 在 org.eclipse.ui.internal.Workbench.lambda$3(Workbench.java:644) 在 org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:338) 在 org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:551) 在 org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:156) 在 org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:152) 在 org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:203) 在 org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:134) 在 org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104) 在 org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:401) 在 org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255) 在 java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke0(本地方法) 在 java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke(未知源) 在 java.base/jdk.internal.reflect.DelegatingMethodAccessorImpl.invoke(未知来源) 在 java.base/java.lang.reflect.Method.invoke(未知来源) 在 org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:654) 在 org.eclipse.equinox.launcher.Main.basicRun(Main.java:591) 在 org.eclipse.equinox.launcher.Main.run(Main.java:1462) 引起:org.eclipse.swt.SWTException: i/o error (java.io.FileNotFoundException: C:\Git\mingw64\share\git\git-for-windows.ico (系统找不到指定的路径。)) 在 org.eclipse.swt.SWT.error(SWT.java:4893) 在 org.eclipse.swt.SWT.error(SWT.java:4808) 在 org.eclipse.swt.graphics.ImageLoader.load(ImageLoader.java:184) 在 org.eclipse.tm.terminal.view.ui.local.showin.ExternalExecutablesUtils.loadImage(ExternalExecutablesUtils.java:38) 在 org.eclipse.tm.terminal.view.ui.local.showin.DynamicContributionItems.getContributionItems(DynamicContributionItems.java:74) 在 org.eclipse.ui.actions.CompoundContributionItem.getContributionItemsToFill(CompoundContributionItem.java:83) 在 org.eclipse.ui.actions.CompoundContributionItem.fill(CompoundContributionItem.java:57) 在 org.eclipse.ui.internal.menus.DynamicMenuContributionItem.fill(DynamicMenuContributionItem.java:146) 在 org.eclipse.jface.action.MenuManager.doItemFill(MenuManager.java:729) 在 org.eclipse.jface.action.MenuManager.update(MenuManager.java:806) 在 org.eclipse.jface.action.MenuManager.update(MenuManager.java:673) 在 org.eclipse.e4.ui.workbench.renderers.swt.MenuManagerRenderer.scheduleManagerUpdate(MenuManagerRenderer.java:1227) 在 org.eclipse.e4.ui.workbench.renderers.swt.MenuManagerRenderer.subscribeUIElementTopicVisible(MenuManagerRenderer.java:213) 在 jdk.internal.reflect.GeneratedMethodAccessor35.invoke(未知来源) 在 java.base/jdk.internal.reflect.DelegatingMethodAccessorImpl.invoke(未知来源) 在 java.base/java.lang.reflect.Method.invoke(未知来源) 在 org.eclipse.e4.core.internal.di.MethodRequestor.execute(MethodRequestor.java:58) 还有 63 个 Caused by: java.io.FileNotFoundException: C:\Git\mingw64\share\git\git-for-windows.ico (系统找不到指定的路径。) 在 java.base/java.io.FileInputStream.open0(Native方法) 在 java.base/java.io.FileInputStream.open(未知来源) 在 java.base/java.io.FileInputStream. (未知)来源) 在 java.base/java.io.FileInputStream. (未知)来源) 在 org.eclipse.swt.graphics.ImageLoader.load(ImageLoader.java:181) 还有77个 Re: [S32DS] eclipse - java.io.FileNotFoundException !? 我找不到任何 `C:\Git\...` 文件。!? CY9_0-1787192155321.pngCY9_0-1787192155321.pngCY9_0-1787192155321.pngCY9_0-1787192155321.png Re: [S32DS] eclipse - java.io.FileNotFoundException !? 嗨@CY9 如错误消息所示,S32DS 无法在配置的位置找到 git-for-windows.ico。请尝试在系统中指向正确的路径。为此,请导航至: 窗口 → 首选项 → 团队 → Git → 配置 → 系统设置 然后更新位置,使其与您计算机上的实际安装路径相匹配。 BR,VaneB Re: [S32DS] eclipse - java.io.FileNotFoundException !? 嗨@CY9 抱歉,我分享错了地点。我之前提到的设置无法编辑。请改用以下方式: 打开“窗口”→“首选项”→“终端”→“本地终端”,勾选“显示在...”自定义条目部分。 您可以在这里查找 Git 路径。 Re: [S32DS] eclipse - java.io.FileNotFoundException !? 正确的 ! 这里是一条空路: CY9_0-1787269588821.pngCY9_0-1787269588821.png [编辑] CY9_1-1787269614644.pngCY9_1-1787269614644.png 案件已结
View full article
RDGD3162I3PH5EVB 与 SiC 功率模块的兼容性 晚上好, UM11802 中指出,RDGD3162I3PH5EVB 与 IGBT 和 SiC 功率模块均兼容。图 9(UM11802)显示了 SiC 功率模块与评估板兼容所需的引脚排列。 我遇到了这个问题:我找不到引脚排列相同的 SiC 功率模块:例如,FS03MR12A6MA1B (SiC) 的引脚排列与 FS950R08A6P2B (IGBT) 类似,但即使忽略第一个源极引脚 S2.2,G2 和 S2.1 引脚的顺序也与 IGBT 功率模块中对应的 E2 和 G2 引脚的顺序相反。此外,G1、S1(SiC)引脚与IGBT的G1和E1引脚相比,存在1个引脚的偏移。 是否有市售的、与 RDGD3162I3PH5EVB 直接兼容的 SiC 功率模块的零件编号? 谢谢, 恩里科 隔离式栅极驱动器 Re: RDGD3162I3PH5EVB compatibility with SiC power module 你好, 我们已经看到模块供应商逐步淘汰了 RDGD3162I3PH5EVB 的确切模块引脚排列,特别是对于 SiC 模块而言。几年前,这种封装形式还有更多选择,但现在这种引脚排列/封装已经逐渐停产了。 今天我们看到了更多像您指出的那样的开尔文连接,以及来自 IFX(如 FS03MR12A7MA2B)和 Starpower 的一些 HybridPack Gen2。 我们更倾向于在新 EVB 中使用量产模块,但我们无法保证模块供应商在我们设计好电路板后未来会采取什么措施。 你已经决定选择GD3162了吗?您是需要用于原型制作的完整PCB,还是最终会自己设计PCB?与我们联系他们的限制条件和项目详情,我们才能想出解决方案。 此致敬礼! Re: RDGD3162I3PH5EVB compatibility with SiC power module 谢谢你的回答。 能否告诉我一个兼容的SiC模块的具体零件编号,即使它已经停产了? 是的,我已经决定要买GD3162了。 谢谢你, 恩里科
View full article
ヘルプ:P2020RDB SCH <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> このCPUのSCHファイルが勉強に必要です。どなたかこのPDFかSCHファイルを送ってもらえますか?ありがとうございます!! QorIQ P2デバイス Re: help:P2020RDB SCH あなたの研究に関する情報やリソース、ドキュメントを見つけるお手伝いを喜んでします。 Re: help:P1020RDB SCH pcb bom そのファイルを渡すことを申し出てくれますか?ありがとう Re: help:P2020RDB SCH <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 添付ファイルをご覧ください。 すてきな一日を、 パベル・チュバコフ ----------------------------------------------------------------------------------------------------------------------- 注:この記事があなたの質問への回答になっている場合は、「正解」ボタンをクリックしてください。ありがとう! -----------------------------------------------------------------------------------------------------------------------
View full article
S32DSライセンスの有効期限が切れました こんにちは、サポートの皆さん 私のS32 Design Studio for ARM v2018 R1ライセンスが期限切れになりました。 この問題を解決するのを手伝ってください。ありがとうございます。 アクティベーションコード:4C0D-B64D-273C-7821 BT Re: S32DS license expired こんにちは、 お客様のS32DSライセンスが延長されました。
View full article
S32DS许可证已过期 您好,客服人员。 我的 S32 Design Studio for ARM v2018 R1 许可证已过期。 请帮我解决这个问题,谢谢。 激活码:4C0D-B64D-273C-7821 BT Re: S32DS license expired 你好, 您的S32DS许可证已延期。
View full article
SJA1105QからSJA1105S こんにちは、 SA1105QをSJA1105Sに交換したいです。ハードウェアやファームウェアを変更せずにこれを実現することは可能でしょうか?SJA1105Sを直接SJA1105Qボードに取り付けてもいいですか? 1. ハードウェア:SJA1105SとSJA1105Qのデータシートを確認したところ、異なっていました。SGMIIデジタル:1.14~1.32V、標準1.2V SJA1105Q: VDD(MII) MII電源標準電圧: 1.8V 2. ファームウェア:ファームウェアBSPの違いは何ですか?変更する必要はありますか? Re: SJA1105Q to SJA1105S こんにちは 既存のSJA1105Q基板では、ポート4は未使用です。L8/L10/L11は既にGNDに接続されています。N12はGNDに紐づいており、N8はNCで、R/S専用のVSSボール(N7、N9、P6、P7)はNCです。ハードウェアの改造なしにこのPCB上で直接組み立てSJA1105SEL可能でしょうか? Re: SJA1105Q to SJA1105S こんにちは、 @Yubang1006 さん。 SJA1105SELは既存のSJA1105Q PCB上で直接組み立てることができません。ハードウェアの改造なしには、ポート4が使われていなくてもです。 SJA1105QとSはピン互換性がありません。PCBは変更する必要があるでしょう。例えばSJA1105S上の専用VSSボールはアースに接続する必要があります。第2章5.1.3未使用のxMIIインターフェースは、未使用のSGMIIをどのように扱うかを指定します。 ファームウェアに関しては、SJA1105QとSJA1105Sは同じスイッチコアデバイスIDを使っています。既存設定でポート4が無効化されており、ソフトウェアがデバイス固有の部品番号を確認したり、ポート4のxMII/SGMIIレジスタにアクセスしない場合、既存のファームウェア構成が適用されたままである場合があります。それでも、ソフトウェアがSJA1105Q部品番号に明確に依存していないか確認する必要があります。 よろしくお願いいたします。 パベル
View full article
帮助:P2020RDB SCH <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 我需要这份CPU原理图文件用于学习,请问有人可以发给我这份PDF或原理图文件吗?谢谢! QorIQ P2 设备 Re: help:P2020RDB SCH 我很乐意帮助您查找学习所需的信息、资源或资料。 Re: help:P1020RDB SCH pcb bom 您能否提供这些文件?谢谢 Re: help:P2020RDB SCH <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 请参阅附件。 祝你有美好的一天, 帕维尔·丘巴科夫 ----------------------------------------------------------------------------------------------------------------------- 注:如果此回复解答了您的问题,请点击“正确答案”按钮。谢谢你! -----------------------------------------------------------------------------------------------------------------------
View full article
[S32DS] eclipse - java.io.FileNotFoundException !? I have no folder named `git` under C:\  My `git-for-windows.ico` file is under  D:\msys64\mingw64\share\git\git-for-windows.ico  Everytime I compiled something, it pop up. It's annoying.  CY9_0-1787121511238.pngCY9_0-1787121511238.pngCY9_0-1787121511238.pngCY9_0-1787121511238.png -- org.eclipse.e4.core.di.InjectionException: org.eclipse.swt.SWTException: i/o error (java.io.FileNotFoundException: C:\Git\mingw64\share\git\git-for-windows.ico (系統找不到指定的路徑。)) at org.eclipse.e4.core.internal.di.MethodRequestor.execute(MethodRequestor.java:68) at org.eclipse.swt.widgets.Synchronizer.syncExec(Synchronizer.java:236) at org.eclipse.ui.internal.UISynchronizer.syncExec(UISynchronizer.java:133) at org.eclipse.swt.widgets.Display.syncExec(Display.java:4742) at org.eclipse.e4.ui.workbench.swt.DisplayUISynchronize.syncExec(DisplayUISynchronize.java:34) at org.eclipse.e4.ui.internal.di.UIEventObjectSupplier$UIEventHandler.handleEvent(UIEventObjectSupplier.java:64) at org.eclipse.equinox.internal.event.EventHandlerWrapper.handleEvent(EventHandlerWrapper.java:205) at org.eclipse.equinox.internal.event.EventHandlerTracker.dispatchEvent(EventHandlerTracker.java:203) at org.eclipse.equinox.internal.event.EventHandlerTracker.dispatchEvent(EventHandlerTracker.java:1) at org.eclipse.osgi.framework.eventmgr.EventManager.dispatchEvent(EventManager.java:234) at org.eclipse.osgi.framework.eventmgr.ListenerQueue.dispatchEventSynchronous(ListenerQueue.java:151) at org.eclipse.equinox.internal.event.EventAdminImpl.dispatchEvent(EventAdminImpl.java:133) at org.eclipse.equinox.internal.event.EventAdminImpl.sendEvent(EventAdminImpl.java:75) at org.eclipse.equinox.internal.event.EventComponent.sendEvent(EventComponent.java:44) at org.eclipse.e4.ui.services.internal.events.EventBroker.send(EventBroker.java:55) at org.eclipse.e4.ui.internal.workbench.UIEventPublisher.notifyChanged(UIEventPublisher.java:63) at org.eclipse.emf.common.notify.impl.BasicNotifierImpl.eNotify(BasicNotifierImpl.java:424) at org.eclipse.e4.ui.model.application.ui.impl.UIElementImpl.setVisible(UIElementImpl.java:361) at org.eclipse.e4.ui.workbench.renderers.swt.ContributionRecord.updateVisibility(ContributionRecord.java:113) at org.eclipse.e4.ui.workbench.renderers.swt.MenuManagerRendererFilter.updateElementVisibility(MenuManagerRendererFilter.java:191) at org.eclipse.e4.ui.workbench.renderers.swt.MenuManagerRendererFilter.updateElementVisibility(MenuManagerRendererFilter.java:202) at org.eclipse.e4.ui.workbench.renderers.swt.MenuManagerShowProcessor.showMenu(MenuManagerShowProcessor.java:256) at org.eclipse.e4.ui.workbench.renderers.swt.MenuManagerShowProcessor.menuAboutToHide(MenuManagerShowProcessor.java:114) at org.eclipse.jface.internal.MenuManagerEventHelper.showEventPostHelper(MenuManagerEventHelper.java:95) at org.eclipse.jface.action.MenuManager.handleAboutToShow(MenuManager.java:469) at org.eclipse.jface.action.MenuManager.access$1(MenuManager.java:463) at org.eclipse.jface.action.MenuManager$2.menuShown(MenuManager.java:495) at org.eclipse.swt.widgets.TypedListener.handleEvent(TypedListener.java:259) at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:89) at org.eclipse.swt.widgets.Display.sendEvent(Display.java:4209) at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1043) at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1067) at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1048) at org.eclipse.swt.widgets.Control.WM_INITMENUPOPUP(Control.java:5157) at org.eclipse.swt.widgets.Control.windowProc(Control.java:4789) at org.eclipse.swt.widgets.Canvas.windowProc(Canvas.java:340) at org.eclipse.swt.widgets.Decorations.windowProc(Decorations.java:1480) at org.eclipse.swt.widgets.Shell.windowProc(Shell.java:2263) at org.eclipse.swt.widgets.Display.windowProc(Display.java:4930) at org.eclipse.swt.internal.win32.OS.TrackPopupMenu(Native Method) at org.eclipse.swt.widgets.Menu._setVisible(Menu.java:237) at org.eclipse.swt.widgets.Display.runPopups(Display.java:4067) at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3620) at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine$5.run(PartRenderingEngine.java:1157) at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:338) at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.run(PartRenderingEngine.java:1046) at org.eclipse.e4.ui.internal.workbench.E4Workbench.createAndRunUI(E4Workbench.java:155) at org.eclipse.ui.internal.Workbench.lambda$3(Workbench.java:644) at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:338) at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:551) at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:156) at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:152) at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:203) at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:134) at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104) at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:401) at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255) at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke0(Native Method) at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke(Unknown Source) at java.base/jdk.internal.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source) at java.base/java.lang.reflect.Method.invoke(Unknown Source) at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:654) at org.eclipse.equinox.launcher.Main.basicRun(Main.java:591) at org.eclipse.equinox.launcher.Main.run(Main.java:1462) Caused by: org.eclipse.swt.SWTException: i/o error (java.io.FileNotFoundException: C:\Git\mingw64\share\git\git-for-windows.ico (系統找不到指定的路徑。)) at org.eclipse.swt.SWT.error(SWT.java:4893) at org.eclipse.swt.SWT.error(SWT.java:4808) at org.eclipse.swt.graphics.ImageLoader.load(ImageLoader.java:184) at org.eclipse.tm.terminal.view.ui.local.showin.ExternalExecutablesUtils.loadImage(ExternalExecutablesUtils.java:38) at org.eclipse.tm.terminal.view.ui.local.showin.DynamicContributionItems.getContributionItems(DynamicContributionItems.java:74) at org.eclipse.ui.actions.CompoundContributionItem.getContributionItemsToFill(CompoundContributionItem.java:83) at org.eclipse.ui.actions.CompoundContributionItem.fill(CompoundContributionItem.java:57) at org.eclipse.ui.internal.menus.DynamicMenuContributionItem.fill(DynamicMenuContributionItem.java:146) at org.eclipse.jface.action.MenuManager.doItemFill(MenuManager.java:729) at org.eclipse.jface.action.MenuManager.update(MenuManager.java:806) at org.eclipse.jface.action.MenuManager.update(MenuManager.java:673) at org.eclipse.e4.ui.workbench.renderers.swt.MenuManagerRenderer.scheduleManagerUpdate(MenuManagerRenderer.java:1227) at org.eclipse.e4.ui.workbench.renderers.swt.MenuManagerRenderer.subscribeUIElementTopicVisible(MenuManagerRenderer.java:213) at jdk.internal.reflect.GeneratedMethodAccessor35.invoke(Unknown Source) at java.base/jdk.internal.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source) at java.base/java.lang.reflect.Method.invoke(Unknown Source) at org.eclipse.e4.core.internal.di.MethodRequestor.execute(MethodRequestor.java:58) ... 63 more Caused by: java.io.FileNotFoundException: C:\Git\mingw64\share\git\git-for-windows.ico (系統找不到指定的路徑。) at java.base/java.io.FileInputStream.open0(Native Method) at java.base/java.io.FileInputStream.open(Unknown Source) at java.base/java.io.FileInputStream. (Unknown Source) at java.base/java.io.FileInputStream. (Unknown Source) at org.eclipse.swt.graphics.ImageLoader.load(ImageLoader.java:181) ... 77 more Re: [S32DS] eclipse - java.io.FileNotFoundException !? I can *NOT* find any `C:\Git\...` exist. !? CY9_0-1787192155321.pngCY9_0-1787192155321.pngCY9_0-1787192155321.pngCY9_0-1787192155321.png Re: [S32DS] eclipse - java.io.FileNotFoundException !? Hi @CY9  As shown in the error message, S32DS is unable to find the git-for-windows.ico in the configured locations. Try pointing to the correct path on your system. To do this, navigate to: Window → Preferences → Team → Git → Configuration → System Settings Then update the location so that it matches the actual installation path on your machine. BR, VaneB Re: [S32DS] eclipse - java.io.FileNotFoundException !? Hi @CY9  Sorry about that, I shared the wrong location. The settings I mentioned previously cannot be edited. Instead, please go to: Window → Preferences → Terminal → Local Terminal and check the "Show In..." Custom Entries section.  This is where you can look for Git paths. Re: [S32DS] eclipse - java.io.FileNotFoundException !? Correct !  It's empty path here :  CY9_0-1787269588821.pngCY9_0-1787269588821.png [Edit]  CY9_1-1787269614644.pngCY9_1-1787269614644.png ~case closed~ 
View full article
S32DS license expired Hi Support My S32 Design Studio for ARM v2018 R1 license has expired. Please help me to solved this problem, thank you. Activation Code: 4C0D-B64D-273C-7821 BT Re: S32DS license expired Hi,  your S32DS license has been extended. 
View full article
SJA1105Q to SJA1105S Hello, I want to replace my SA1105Q with an SJA1105S. Is this possible without changing the hardware and firmware? Can I directly mount the SJA1105S onto the SJA1105Q board? 1. Hardware: I checked the datasheets for the SJA1105S and SJA1105Q and found they are different. SGMII Digital: 1.14~1.32V, typical 1.2V SJA1105Q: VDD(MII) MII Supply typical Voltage: 1.8V 2. Firmware: What are the differences in the firmware BSP? Do I need to modify it? Re: SJA1105Q to SJA1105S Hello On our existing SJA1105Q PCB, Port 4 is unused. L8/L10/L11 are already tied to GND. N12 is tied to GND, while N8 is NC, and some R/S-only VSS balls (N7, N9, P6, P7) are NC. Can SJA1105SEL be directly assembled on this PCB without hardware modification? Re: SJA1105Q to SJA1105S Hello @Yubang1006 , The SJA1105SEL cannot be directly assembled on the existing SJA1105Q PCB without hardware modification, even if Port 4 is unused. SJA1105Q and S are not pin compatible. The PCB would need to be modified, e.g. dedicated VSS balls on the SJA1105S must be connected to ground. Chapter 2.5.1.3 Unused xMII Interface specifies how unused SGMII shall be handled. Regarding firmware, the SJA1105Q and SJA1105S use the same switch-core device ID. If Port 4 is already disabled in the existing configuration and the software does not check the device-specific part number or access the Port 4 xMII/SGMII registers, the existing firmware configuration may remain applicable. Nevertheless, the software should be checked for any explicit dependency on the SJA1105Q part number. Best regards, Pavel
View full article
RDGD3162I3PH5EVB compatibility with SiC power module Good evening,  In the UM11802 is stated that the RDGD3162I3PH5EVB is compatible both with IGBT and SiC power modules. In UM11802, figure 9, is shown the pinout a SiC power module shoud have to be compatible with the evaluation board.  I'm facing this problem: I can't find a SiC power module that has that same pinout: for example, the FS03MR12A6MA1B (SiC) has a similar pinout to the FS950R08A6P2B (IGBT), but even ignoring the first source pin S2.2, the G2 and S2.1 pins are in an inverted order compared to the corrisponding E2 and G2 pins shown in the IGBT power module. Also G1, S1 (SiC) have a 1 position offset compared to the G1 and E1 pins for the IGBT.  Is there a commercially available part number for a SiC power module that is directly compatible with the RDGD3162I3PH5EVB? Thanks,  Enrico Isolated Gate Drivers Re: RDGD3162I3PH5EVB compatibility with SiC power module Hello, We have seen the RDGD3162I3PH5EVB's exact module pinout get phased out by module suppliers, particularly for SiC. Some years ago there were more options with this footprint, but this pinout/package is slowly EOLed by now. Today we see more kelvin connections like you pointed out, and some HybridPack Gen2 from IFX (like the FS03MR12A7MA2B) and Starpower. We prefer to use production modules for our new EVBs but we can't guarantee what the module suppliers will do in future after we design the board. Are you already set on GD3162? Are you needing a fully-done PCB for prototyping or will you design your own PCB eventually? Let us know their constraints and project details and we can think of a solution. Regards! Re: RDGD3162I3PH5EVB compatibility with SiC power module Thank you for your answer.  Could you point me out a specific part number for a compatible SiC module, even if it's not in production anymore? Yes, I'm already set on the GD3162. Thank you,  Enrico
View full article
SJA1105Q 至 SJA1105S 你好, 我想用 SJA1105S 替换我的 SA1105Q。不更改硬件和固件是否可以实现?我可以直接将 SJA1105S 安装到 SJA1105Q 板上吗? 1. 硬件:我查看了 SJA1105S 和 SJA1105Q 的数据手册,发现它们有所不同。SGMII 数字:1.14~1.32V,典型值 1.2V SJA1105Q:VDD(MII) MII 供电典型电压:1.8V 2. 固件:固件电路板支持包之间有什么区别?我需要修改它吗? Re: SJA1105Q to SJA1105S 你好 在我们现有的 SJA1105Q PCB 上,端口 4 未使用。L8/L10/L11 已接地。N12 连接到 GND,而 N8 为 NC,一些仅 R/S 的 VSS 球(N7、N9、P6、P7)为 NC。SJA1105SEL能否直接组装到这块PCB板上,而无需进行硬件修改? Re: SJA1105Q to SJA1105S 你好@Yubang1006 , 即使端口 4 未使用,SJA1105SEL 也不能在不进行硬件修改的情况下直接组装到现有的 SJA1105Q PCB 上。 SJA1105Q 和 S 的引脚不兼容。需要对PCB进行修改,例如SJA1105S 上的专用 VSS 球必须接地。第 2.5.1.3 章未使用的 xMII 接口规定了如何处理未使用的 SGMII。 关于固件,SJA1105Q 和 SJA1105S 使用相同的交换机核心设备 ID。如果端口 4 在现有配置中已被禁用,并且软件不检查设备特定的部件号或访问端口 4 xMII/SGMII 寄存器,则现有固件配置可能仍然适用。不过,还是应该检查一下软件是否对 SJA1105Q 部件号有任何显式依赖关系。 顺祝商祺! 帕维尔
View full article
[S32DS] eclipse - java.io.FileNotFoundException !? C:\ の下に `git` という名前のフォルダがありません。 私の`git-for-windows.ico`ファイルは D:\msys64\mingw64\share\git\git-for-windows.ico にあります 何かをコンパイルするたびに、それがポップアップ表示されます。 イライラする。 CY9_0-1787121511238.pngCY9_0-1787121511238.pngCY9_0-1787121511238.pngCY9_0-1787121511238.png -- org.eclipse.e4.core.di.InjectionException: org.eclipse.swt.SWTException: i/o エラー (java.io.FileNotFoundException: C:\Git\mingw64\share\git\git-for-windows.ico (系統找不到指定的路徑。)) org.eclipse.e4.core.internal.di.MethodRequestor.execute(MethodRequestor.java:68) で発生 org.eclipse.swt.widgets.Synchronizer.syncExec(Synchronizer.java:236) で発生 org.eclipse.ui.internal.UISynchronizer.syncExec(UISynchronizer.java:133) で発生 org.eclipse.swt.widgets.Display.syncExec(Display.java:4742) で発生 org.eclipse.e4.ui.workbench.swt.DisplayUISynchronize.syncExec(DisplayUISynchronize.java:34) で発生 org.eclipse.e4.ui.internal.di.UIEventObjectSupplier$UIEventHandler.handleEvent(UIEventObjectSupplier.java:64) at org.eclipse.equinox.internal.event.EventHandlerWrapper.handleEvent(EventHandlerWrapper.java:205) at org.eclipse.equinox.internal.event.EventHandlerTracker.dispatchEvent(EventHandlerTracker.java:203) at org.eclipse.equinox.internal.event.EventHandlerTracker.dispatchEvent(EventHandlerTracker.java:1) org.eclipse.osgi.framework.eventmgr.EventManager.dispatchEvent(EventManager.java:234) で org.eclipse.osgi.framework.eventmgr.ListenerQueue.dispatchEventSynchronous(ListenerQueue.java:151) で発生 at org.eclipse.equinox.internal.event.EventAdminImpl.dispatchEvent(EventAdminImpl.java:133) at org.eclipse.equinox.internal.event.EventAdminImpl.sendEvent(EventAdminImpl.java:75) at org.eclipse.equinox.internal.event.EventComponent.sendEvent(EventComponent.java:44) at org.eclipse.e4.ui.services.internal.events.EventBroker.send(EventBroker.java:55) org.eclipse.e4.ui.internal.workbench.UIEventPublisher.notifyChanged(UIEventPublisher.java:63) で発生 org.eclipse.emf.common.notify.impl.BasicNotifierImpl.eNotify(BasicNotifierImpl.java:424) で発生 at org.eclipse.e4.ui.model.application.ui.impl.UIElementImpl.setVisible(UIElementImpl.java:361) org.eclipse.e4.ui.workbench.renderers.swt.ContributionRecord.updateVisibility(ContributionRecord.java:113) で発生 org.eclipse.e4.ui.workbench.renderers.swt.MenuManagerRendererFilter.updateElementVisibility(MenuManagerRendererFilter.java:191) で発生 org.eclipse.e4.ui.workbench.renderers.swt.MenuManagerRendererFilter.updateElementVisibility(MenuManagerRendererFilter.java:202) で発生 org.eclipse.e4.ui.workbench.renderers.swt.MenuManagerShowProcessor.showMenu(MenuManagerShowProcessor.java:256) で発生 org.eclipse.e4.ui.workbench.renderers.swt.MenuManagerShowProcessor.menuAboutToHide(MenuManagerShowProcessor.java:114) で発生 org.eclipse.jface.internal.MenuManagerEventHelper.showEventPostHelper(MenuManagerEventHelper.java:95) で発生 org.eclipse.jface.action.MenuManager.handleAboutToShow(MenuManager.java:469) で発生 org.eclipse.jface.action.MenuManager.access$1(MenuManager.java:463) で発生 org.eclipse.jface.action.MenuManager$2.menuShown(MenuManager.java:495) で発生 org.eclipse.swt.widgets.TypedListener.handleEvent(TypedListener.java:259) で発生 org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:89) で発生 org.eclipse.swt.widgets.Display.sendEvent(Display.java:4209) で発生 org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1043) で発生 org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1067) で発生 org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1048) で発生 org.eclipse.swt.widgets.Control.WM_INITMENUPOPUP(Control.java:5157) で発生 org.eclipse.swt.widgets.Control.windowProc(Control.java:4789) で発生 org.eclipse.swt.widgets.Canvas.windowProc(Canvas.java:340) で発生 org.eclipse.swt.widgets.Decorations.windowProc(Decorations.java:1480) で発生 org.eclipse.swt.widgets.Shell.windowProc(Shell.java:2263) で発生 org.eclipse.swt.widgets.Display.windowProc(Display.java:4930) で発生 at org.eclipse.swt.internal.win32.OS.TrackPopupMenu(Native 方法) org.eclipse.swt.widgets.Menu._setVisible(Menu.java:237) で発生 org.eclipse.swt.widgets.Display.runPopups(Display.java:4067) で発生 org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3620) で発生 org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine$5.run(PartRenderingEngine.java:1157) で発生 org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:338) で発生 org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.run(PartRenderingEngine.java:1046) で発生 org.eclipse.e4.ui.internal.workbench.E4Workbench.createAndRunUI(E4Workbench.java:155) でエラーが発生しました。 org.eclipse.ui.internal.Workbench.lambda$3(Workbench.java:644) で発生 org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:338) で発生 org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:551) でエラーが発生しました。 org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:156) でエラーが発生しました。 at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:152) org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:203) で発生 org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:134) で発生 org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104) で発生 org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:401) でエラーが発生しました。 org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255) で発生 at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke0(Native Method) at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke(Unknown Source) java.base/jdk.internal.reflect.DelegatingMethodAccessorImpl.invoke(Unknown) でソース) java.base/java.lang.reflect.Method.invoke(Unknown)ソース) org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:654) で発生 org.eclipse.equinox.launcher.Main.basicRun(Main.java:591) で発生 org.eclipse.equinox.launcher.Main.run(Main.java:1462) で発生 原因: org.eclipse.swt.SWTException: i/o エラー (java.io.FileNotFoundException: C:\Git\mingw64\share\git\git-for-windows.ico (系統找不到指定的路徑。)) org.eclipse.swt.SWT.error(SWT.java:4893) でエラーが発生しました。 org.eclipse.swt.SWT.error(SWT.java:4808) でエラーが発生しました。 org.eclipse.swt.graphics.ImageLoader.load(ImageLoader.java:184) で発生 org.eclipse.tm.terminal.view.ui.local.showin.ExternalExecutablesUtils.loadImage(ExternalExecutablesUtils.java:38) でエラーが発生しました。 org.eclipse.tm.terminal.view.ui.local.showin.DynamicContributionItems.getContributionItems(DynamicContributionItems.java:74) で発生 org.eclipse.ui.actions.CompoundContributionItem.getContributionItemsToFill(CompoundContributionItem.java:83) で発生 org.eclipse.ui.actions.CompoundContributionItem.fill(CompoundContributionItem.java:57) で発生 org.eclipse.ui.internal.menus.DynamicMenuContributionItem.fill(DynamicMenuContributionItem.java:146) org.eclipse.jface.action.MenuManager.doItemFill(MenuManager.java:729) で org.eclipse.jface.action.MenuManager.update(MenuManager.java:806) で発生 org.eclipse.jface.action.MenuManager.update(MenuManager.java:673) で発生 org.eclipse.e4.ui.workbench.renderers.swt.MenuManagerRenderer.scheduleManagerUpdate(MenuManagerRenderer.java:1227) org.eclipse.e4.ui.workbench.renderers.swt.MenuManagerRenderer.subscribeUIElementTopicVisible(MenuManagerRenderer.java:213) で発生 jdk.internal.reflect.GeneratedMethodAccessor35.invoke(Unknown) で実行ソース) java.base/jdk.internal.reflect.DelegatingMethodAccessorImpl.invoke(Unknown) でソース) java.base/java.lang.reflect.Method.invoke(Unknown)ソース) org.eclipse.e4.core.internal.di.MethodRequestor.execute(MethodRequestor.java:58) で発生 ...さらに63件 原因: java.io.FileNotFoundException: C:\Git\mingw64\share\git\git-for-windows.ico (系統が指定されていない路徑。) at java.base/java.io.FileInputStream.open0(Native方法) at java.base/java.io.FileInputStream.open(Unknownソース) at java.base/java.io.FileInputStream. (Unknownソース) at java.base/java.io.FileInputStream. (Unknownソース) org.eclipse.swt.graphics.ImageLoader.load(ImageLoader.java:181) で発生 ...さらに77件 Re: [S32DS] eclipse - java.io.FileNotFoundException !? 「C:\Git\...」という言葉は*全く*見つかりません。!? CY9_0-1787192155321.pngCY9_0-1787192155321.pngCY9_0-1787192155321.pngCY9_0-1787192155321.png Re: [S32DS] eclipse - java.io.FileNotFoundException !? こんにちは@CY9 エラーメッセージに示されているように、S32DS は設定された場所に git-for-windows.ico を見つけることができません。システム上の正しいパスを指定してみてください。これを行うには、次の場所に移動してください。 ウィンドウ → 環境設定 → チーム → Git → 構成 → システム設定 その後、実際のインストール経路と一致するように場所を更新してください。 BR、VaneB Re: [S32DS] eclipse - java.io.FileNotFoundException !? こんにちは@CY9 申し訳ありません、間違った場所を共有してしまいました。先ほど述べた設定は編集できません。代わりに、こちらへアクセスしてください。 ウィンドウ → 環境設定 → ターミナル → ローカルターミナルを開き、「表示場所」の「カスタムエントリ」セクションにチェックを入れてください。 ここでGitパスを探すことができます。 Re: [S32DS] eclipse - java.io.FileNotFoundException !? 正しい ! ここは空の道です。 CY9_0-1787269588821.pngCY9_0-1787269588821.png [編集] CY9_1-1787269614644.pngCY9_1-1787269614644.png ~事件は解決~
View full article