2406384_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2406384_en-US

2406384_en-US

The program malfunctioned after encryption with imxrt1050 bee.

The program is simply a timer program that makes an LED blink. It runs normally on an unencrypted board, but it doesn't run on an encrypted board after encryption. I don't know how to troubleshoot this. The J-Link can't connect either, making troubleshooting even more difficult. I'm using AXF or HEX image files. In the program used by FDCB, because the DQS pin is used, QSPI is set to 50M, and CSStepUp/Hold is set to 2. Snipaste_2026-08-19_11-10-50.pngSnipaste_2026-08-19_11-10-50.pngSnipaste_2026-08-19_11-10-50.png Snipaste_2026-08-19_11-11-26.pngSnipaste_2026-08-19_11-11-26.pngSnipaste_2026-08-19_11-11-26.png Snipaste_2026-08-19_11-12-16.pngSnipaste_2026-08-19_11-12-16.pngSnipaste_2026-08-19_11-12-16.png

i.MXRT 105xRe: imxrt1050 bee加密后程序运行异常

Hi @ccc_clive ,


I noticed you're using OTPMK, which is the SNVS key, as the key. However, this key is only valid when HAB is closed; otherwise, it's all zeros. Try the signed encrypted XIP mode to see if you get a different result.


Additionally, our experts have discussed similar situations in previous articles; for details, please refer to "If i.MXRT1xxx fails to start offline, please first check the SRC_SBMRx register".


Best Regards,

Kan

Re: imxrt1050 bee加密后程序运行异常You can erase everything and re-download, but it won't look like anything has changed.Re: imxrt1050 bee加密后程序运行异常

Hi @ccc_clive ,


Can you change the board's boot mode to serial download? If so, use SPT or MCUBootUtilities to perform a mass erase and see if you can re-flash the image.


Best Regards,

Kan

タグ(1)
評価なし
バージョン履歴
最終更新日:
木曜日
更新者: