Hello,
I plan to use the I2C4 module of the S32G399 to configure an external PMIC. I would like to ask if this I2C4 module can be configured at a low level via the A core (e.g., clock frequency, pull-up/pull-down resistors, address, etc.)? We will not be using the M core for now. Therefore, we want to use the A core for low-level I/O configuration of the S32G.
MichaelTao_0-1788251860175.pngMichaelTao_0-1788251860175.pngMichaelTao_0-1788251860175.png
Hello, @MichaelTao
Hello, yes, it is possible. The A core can be configured with the I2C4 module.
BR
Chenyin
you may try with s32 design studio for I2C low level driver configuration