Hi NXP Community,
I am working on an edge AI application for the KW45B41Z-EVK (Cortex-M33) and would like advice on deploying a machine learning model on this board.
Since the KW45 SDK does not include the eIQ/TFLM middleware by default, my plan is:
Model Training: Train an n-class classification model for time-series data using eIQ Time Series Studio (eIQ TSS). Since the KW45 is not listed as a target in eIQ TSS, I selected the FRDM-MCXN947 (Cortex-M33) as the target platform to export the model.
Runtime Deployment: Port the middleware/eiq/tensorflow-lite folder from the FRDM-MCXN947 SDK into my KW45 SDK project and link it with CMSIS-NN.
My Questions:
Is porting the eIQ TFLM middleware from the MCXN947 SDK to the KW45 SDK a valid and supported approach?
Is selecting the FRDM-MCXN947 in eIQ TSS suitable for generating models to run on the KW45?
Is there any other recommended or native workflow to implement AI/ML on the KW45B41Z-EVK?
Thanks for your help!
Hi NXP Support Team & Community,
I am writing to follow up on this inquiry, as finding a resolution is quite urgent for my current project timeline.
Could someone from the NXP team please provide a quick confirmation on whether porting the eIQ/TFLM middleware from the FRDM-MCXN947 SDK over to the KW45 SDK is a valid and supported workaround? Any brief guidance or confirmation on the recommended workflow would be extremely helpful so I can confidently proceed with development.
Thank you in advance for your time and assistance!
Hello @Srushti_Mulimani , hope you are doing well.
If you are using eIQ Time Series Studio (TSS), I would recommend porting your project from the FRDM-MCXW71 instead. It is an officially supported target in eIQ TSS and is software compatible with the KW45. Both devices share the same Cortex-M33 core architecture and a similar memory profile, so the generated library should be a much closer match for your hardware.
When using a device with such a different hardware profile as the FRDM-MCXN947 as a target for porting, there is a risk of generating incompatible models, for example, due to the differences in available RAM between both devices, or the generation of NPU-accelerated models specific to the MCXN947.
Hope this helps!
Best regards,
Sofia.