Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
imx8mmini sai1 max sample rates hi     sai1 connect a codecs support sample rates 768khz/32bit. SAI1-RX0 connect codec_DOUT. have no data with 768khz/32bit and L/R channels to read.but SAI1-TXFS/SAI1-TXC could output 768khz/49.152Mhz. read L/R channels with 768khz/16bit and 384khz/32bit is ok.kernel version 6.1.36. thanks. Re: imx8mmini sai1 max sample rates about codecs dts as below: sofia_0571_0-1784080120640.png run arecord cmd with "-f S32_LE -r 384000 -c 2 -d 1 test.wav" or "-f S16_LE -r 786000 -c 2 -d 1 test.wav" is ok. but run with "-f S32_LE -r 768000 -c 2 -d 1 test.wav",test.wav is NULL. Re: imx8mmini sai1 max sample rates Hello, Could you please share your device tree configuration? Which CODEC are you using? Best regards. Re: imx8mmini sai1 max sample rates Hello, If you are getting errors related to the sample rate, could be caused by clock source since it is not able to generate the necessary frequency for that sample rate. Sometimes, is needed to use a dedicated clock source such as an external clock to get an specific sample rate. Best regards. Re: imx8mmini sai1 max sample rates when read with 768kHz 32bit x 2 channel,SAI1_TXFS/SAI1_TXC output is ok(768khz/49.152Mhz),The codec data output pin (connect to SAI1_RX0)has data output when checked with an oscilloscope.Is it possible that imx8mmini sdma is not worKing? Re: imx8mmini sai1 max sample rates Hello, Do you get underflow or overflow errors during testing? Best regards. Re: imx8mmini sai1 max sample rates get kernel print errors during testing as below: [ 506.336480] [858] wait_for_avail:1936: asoc-simple-card sound-pcmdev: capture write error (DMA or IRQ trouble?) Re: imx8mmini sai1 max sample rates Hello, Please share your dmesg: dmesg | grep -i -E "xrun|overrun|dma|fifo|sdma|sai" With that error log the issue could be caused by an overrun, please try to increase period and buffer size, for example: arecord -D hw:0,0 -f S32_LE -r 768000 -c 2 --buffer-size=65536 --period-size=8192 -d 5 test.wav Best regards. Re: imx8mmini sai1 max sample rates hi JorgeCas:  thanks for your reply. the same error when  increase period and buffer size. ------------------------------------ root@mx8mm:/tmp# arecord -v -D hw:0,0 -f S16_LE -r 768000 -c 2 -d 1 test.wav Recording WAVE 'test.wav' : Signed 16 bit Little Endian, Rate 768000 Hz, Stereo Hardware PCM card 0 'pcmdev-audio' device 0 subdevice 0 Its setup is: stream : CAPTURE access : RW_INTERLEAVED format : S16_LE subformat : STD channels : 2 rate : 768000 exact rate : 768000 (768000/1) msbits : 16 buffer_size : 131064 period_size : 16383 period_time : 21332 tstamp_mode : NONE tstamp_type : MONOTONIC period_step : 1 avail_min : 16383 period_event : 0 start_threshold : 1 stop_threshold : 131064 silence_threshold: 0 silence_size : 0 boundary : 9222809086901354496 appl_ptr : 0 hw_ptr : 0 root@mx8mm:/tmp# ls test.wav -la -rw-r--r-- 1 root root 3072044 Jul 22 22:09 test.wav root@mx8mm:/tmp# arecord -D hw:0,0 -f S32_LE -r 768000 -c 2 --buffer-size=65536 --period-size=8192 -d 5 test.wav Recording WAVE 'test.wav' : Signed 32 bit Little Endian, Rate 768000 Hz, Stereo arecord: pcm_read:2221: read error: Input/output error root@mx8mm:/tmp# dmesg | grep -i -E "xrun|overrun|dma|fifo|sdma|sai" [ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000b8400000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node vdevbuffer@b8400000, compatible id shared-dma-pool [ 0.000000] DMA [mem 0x0000000040000000-0x00000000bfffffff] [ 0.000000] DMA32 empty [ 0.000000] Policy zone: DMA [ 0.043871] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations [ 0.044176] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations [ 0.044364] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations [ 0.105243] iommu: DMA domain TLB invalidation policy: strict mode [ 0.195002] imx-sdma 302c0000.dma-controller: Direct firmware load for imx/sdma/sdma-imx7d.bin failed with error -2 [ 0.195018] imx-sdma 302c0000.dma-controller: Falling back to sysfs fallback for: imx/sdma/sdma-imx7d.bin [ 0.199761] mxs-dma 33000000.dma-controller: initialized [ 1.996379] mmc2: SDHCI controller on 30b60000.mmc [30b60000.mmc] using ADMA [ 2.786360] mmc1: SDHCI controller on 30b50000.mmc [30b50000.mmc] using ADMA [ 8.812860] imx-sdma 302c0000.dma-controller: firmware found. [ 8.818748] imx-sdma 30bd0000.dma-controller: firmware found. [ 8.825901] imx-sdma 30bd0000.dma-controller: loaded firmware 4.6 [ 91.326700] [857] soc_hw_sanity_check:775: 30010000.sai-pcmdevice-codec: ASoC: pcmdevice-codec <-> 30010000.sai info: [ 91.326722] [857] soc_hw_sanity_check:777: 30010000.sai-pcmdevice-codec: ASoC: rate mask 0x154c0 [ 91.326728] [857] soc_hw_sanity_check:778: 30010000.sai-pcmdevice-codec: ASoC: ch min 2 max 8 [ 91.326734] [857] soc_hw_sanity_check:780: 30010000.sai-pcmdevice-codec: ASoC: rate min 44100 max 768000 [ 91.342776] [857] fsl_sai_set_bclk:460: fsl-sai 30010000.sai: ratio 2 for freq 24576000Hz based on clock 49152000Hz [ 91.342784] [857] fsl_sai_set_bclk:481: fsl-sai 30010000.sai: best fit: clock id=1, div=2, deviation =0 [ 91.343315] [857] dapm_update_dai_unlocked:2698: fsl-sai 30010000.sai: Update DAI routes for 30010000.sai capture [ 113.965788] [861] soc_hw_sanity_check:775: 30010000.sai-pcmdevice-codec: ASoC: pcmdevice-codec <-> 30010000.sai info: [ 113.965809] [861] soc_hw_sanity_check:777: 30010000.sai-pcmdevice-codec: ASoC: rate mask 0x154c0 [ 113.965816] [861] soc_hw_sanity_check:778: 30010000.sai-pcmdevice-codec: ASoC: ch min 2 max 8 [ 113.965822] [861] soc_hw_sanity_check:780: 30010000.sai-pcmdevice-codec: ASoC: rate min 44100 max 768000 [ 113.977610] [861] fsl_sai_set_bclk:460: fsl-sai 30010000.sai: ratio 1 for freq 49152000Hz based on clock 49152000Hz [ 113.977618] [861] fsl_sai_set_bclk:481: fsl-sai 30010000.sai: best fit: clock id=1, div=1, deviation =0 [ 113.978149] [861] dapm_update_dai_unlocked:2698: fsl-sai 30010000.sai: Update DAI routes for 30010000.sai capture [ 124.127055] [861] wait_for_avail:1936: asoc-simple-card sound-pcmdev: capture write error (DMA or IRQ trouble?) root@mx8mm:/tmp# ls test.wav -la -rw-r--r-- 1 root root 44 Jul 22 22:09 test.wav root@mx8mm:/tmp#
View full article
S32K312 上的 Fat 文件系统集成(RTD 6.0.0,非AUTOSAR、SPI SD卡驱动程序) 您好, 我已经成功地在 S32K312 EVB 上使用 RTD 6.0.0(非 AUTOSAR Lpspi_Ip 驱动程序)实现了通过 SPI 的 SD 卡驱动程序。 以下功能已实现: SD卡初始化(CMD0、CMD8、ACMD41、CMD58) 单块读取(CMD17) 单块写入(CMD24) 多块读取(CMD18) 多块写入(CMD25) 已通过向 SD 卡写入数据并成功读取数据验证了驱动程序。 现在我想添加对 FAT 文件系统的支持,以便在 PC 上创建、写入和读取文件。 我有几个问题: NXP 是否为使用 RTD 6.0.0(非 AUTOSAR)的 S32K312 提供或支持 FatFs 集成?如果没有,是否有其他 S32K3 设备的示例可供参考? NXP是否有任何中间件软件包可以将FatFs与SD卡集成? 如果没有官方示例,建议的方法是集成 Elm-Chan FatFs 库并实现所需的 diskio.c 函数。使用我现有的SD卡驱动程序进行接口? 是否有任何参考项目、应用笔记或示例库演示了在 S32K3 设备上集成 FAT 文件系统? 我有点困惑,不知道哪种方法更适合产品开发。任何指导或参考资料都将不胜感激。 谢谢! Re: Fat Filesystem Integration on S32K312 (RTD 6.0.0, Non-AUTOSAR, SPI SD Card Driver) 嗨@parvathitp 目前 S32K312 尚不支持 FatFS 文件系统。在 S32K3 系列中,FatFS 集成仅适用于包含 uSDHC 外设的设备,该外设提供微控制器和 SD 卡之间的硬件接口。 对于这些设备,我们提供了一个 SDHC 软件栈,通过 uSDHC 驱动程序简化对 SD 总线的访问,并实现与 FatFS 的集成。 社区帖子“将 FatFs 文件系统移植到 KL26 SPI SD 卡代码”中描述的方法和概念可能对您的实现有所帮助。虽然该示例基于 KL26 设备,但正如标题所示,它描述了如何将 FatFS 文件系统移植到不包含 SDHC/uSDHC 外围设备的设备上,这与您的用例类似。 BR,VaneB
View full article
Fat Filesystem Integration on S32K312 (RTD 6.0.0, Non-AUTOSAR, SPI SD Card Driver) Hi, I have successfully implemented an SD Card driver over SPI on the S32K312 EVB using RTD 6.0.0 (Non-AUTOSAR Lpspi_Ip driver). The following functionality is already working: SD card initialization (CMD0, CMD8, ACMD41, CMD58) Single block read (CMD17) Single block write (CMD24) Multiple block read (CMD18) Multiple block write (CMD25) The driver has been verified by successfully writing data to the SD card and reading it back. Now I would like to add FAT filesystem support so that files can be created, written, and read on a PC. I have a few questions: Does NXP provide or support FatFs integration for the S32K312 using RTD 6.0.0 (Non-AUTOSAR)? If not, are there any supported examples available for other S32K3 devices that can be used as a reference? Is there any middleware package from NXP for integrating FatFs with an SD card? If there is no official example, is the recommended approach to integrate the Elm-Chan FatFs library and implement the required diskio.c interface using my existing SD card driver? Are there any reference projects, application notes, or example repositories that demonstrate FAT filesystem integration on S32K3 devices? I am a bit confused about which approach is recommended for production development. Any guidance or references would be greatly appreciated. Thank you. Re: Fat Filesystem Integration on S32K312 (RTD 6.0.0, Non-AUTOSAR, SPI SD Card Driver) Hi @parvathitp  There is currently no specific FatFS support for the S32K312. Within the S32K3 family, FatFS integration is available only for devices that include the uSDHC peripheral, which provides the hardware interface between the microcontroller and an SD card. For these devices, an SDHC software stack is provided to simplify access to the SD bus through the uSDHC driver and to enable integration with FatFS. The approach and concepts described in the community thread "Porting FatFs file system to KL26 SPI SD card code" may be a useful reference for your implementation. Although the example is based on the KL26 device, as the title suggests, it describes how to port the FatFS file system to a device that does not include an SDHC/uSDHC peripheral, which is similar to your use case. BR, VaneB
View full article
构建 Yocto Linux 时出现基础文件错误 构建 Yocto 错误。当我按照 NXP 的 Yocto 指南进行版本时。如何修复此错误? 警告:失败的 setscene 任务的日志文件位于 /home/vmc/Desktop/imx-yocto-bsp/build-wayland/tmp/work/armv8a-poky-linux/ptest-runner/2.4.5+git/temp/log.do_package_setscene.1680451 警告:场景设置任务(/home/vmc/Desktop/imx-yocto-bsp/sources/poky/meta/recipes-support/ptest-runner/ptest-runner_2.4.5.bb:do_package_setscene)执行失败,退出代码为“1”——将改为运行实际任务。 错误:base-files-3.0.14-r0 do_package:执行 exec_func_python() 自动生成的 Python 函数时出错: 导致此异常/失败的 Python 调用堆栈跟踪如下: 文件:'exec_func_python() autogenerated',行号:2,函数: 0001: *** 0002:perform_packagecopy(d) 0003: 文件:'/home/vmc/Desktop/imx-yocto-bsp/sources/poky/meta/classes-global/package.bbclass',行号:363,函数:perform_packagecopy 0359: rpath_replace (dvar, d) 0360:} 0361:perform_packagecopy[cleandirs] = "${PKGD} " 0362:perform_packagecopy[dirs] = "${PKGD} " *** 0363: 0364:python populate_packages() { 0365: oe.package.populate_packages(d) 0366:} 0367:populate_packages[dirs] = " ${D} " 文件:'/usr/lib/python3.10/subprocess.py'行号:421,函数:check_output 0417:否则: 0418:空 = b'' 0419: kwargs['input'] = 空 0420: *** 0421: 返回 run(*popenargs, stdout=PIPE, timeout=timeout, check=True, 0422: **kwargs).stdout 0423: 0424: 0425:class CompletedProcess(object): 文件:'/usr/lib/python3.10/subprocess.py'lineno: 526, function: run 0522: # 我们不调用 process.wait()作为。 __exit__它能帮我们做到这一点。 0523:提高 0524: retcode = process.poll() 0525:如果检查并返回代码: *** 0526: 引发 CalledProcessError(retcode, process.args, 0527: output=stdout, stderr=stderr) 0528: 返回 CompletedProcess(process.args, retcode, stdout, stderr) 0529: 0530: 异常:subprocess.CalledProcessError:命令“tar --exclude=./sysroot-only”-cf - -C /home/vmc/Desktop/imx-yocto-bsp/build-wayland/tmp/work/imx8mqevk-poky-linux/base-files/3.0.14/image -p -S .| tar -xf - -C /home/vmc/Desktop/imx-yocto-bsp/build-wayland/tmp/work/imx8mqevk-poky-linux/base-files/3.0.14/代码包,软件包' 返回非零退出状态 2。 子进程输出: 获取到未知目录的 *at() 系统调用,文件描述符为 4 fd 4 的 bin 路径未知 无法为“bin”分配绝对路径。 tar:./usr/bin:无法创建目录:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径库 无法为“lib”分配绝对路径。 tar:./usr/lib:无法创建目录:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 fd 4 的未知基本路径,路径游戏 无法为“games”分配绝对路径。 tar:./usr/games:无法创建目录:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径共享 无法为“share”分配绝对路径。 tar:./usr/share:无法创建目录:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径共享 无法为“share”分配绝对路径。 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径共享 无法为“share”分配绝对路径。 tar:./usr/share:无法创建目录:地址错误 tar:./usr/share/dict:无法创建目录:没有该文件或目录 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径共享 无法为“share”分配绝对路径。 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径共享 无法为“share”分配绝对路径。 tar:./usr/share:无法创建目录:地址错误 tar: ./usr/share/man:无法创建目录:没有该文件或目录 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径共享 无法为“share”分配绝对路径。 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径共享 无法为“share”分配绝对路径。 tar:./usr/share:无法创建目录:地址错误 tar:./usr/share/doc:无法创建目录:没有该文件或目录 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径共享 无法为“share”分配绝对路径。 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径共享 无法为“share”分配绝对路径。 tar:./usr/share:无法创建目录:地址错误 焦油:./usr/share/doc/base-files-3.0.14:无法创建目录:没有该文件或目录 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径共享 无法为“share”分配绝对路径。 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径共享 无法为“share”分配绝对路径。 tar:./usr/share:无法创建目录:地址错误 tar:./usr/share/misc:无法创建目录:没有该文件或目录 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径共享 无法为“share”分配绝对路径。 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径共享 无法为“share”分配绝对路径。 tar:./usr/share:无法创建目录:地址错误 tar: ./usr/share/common-licenses:无法创建目录:没有该文件或目录 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径共享 无法为“share”分配绝对路径。 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径共享 无法为“share”分配绝对路径。 tar:./usr/share:无法创建目录:地址错误 tar:./usr/share/info:无法创建目录:没有该文件或目录 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的 sbin 路径未知 无法为“sbin”分配绝对路径。 tar:./usr/sbin:无法创建目录:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的源路径未知 无法为“src”分配绝对路径。 tar:./usr/src:无法创建目录:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径包含 无法为“include”分配绝对路径。 tar:./usr/include:无法创建目录:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径 tmp 无法为“tmp”分配绝对路径。 tar:./var/tmp:无法创建指向“volatile/tmp”的符号链接:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的基本路径未知,路径为本地路径 无法为“local”分配绝对路径。 tar:./var/local:无法创建目录:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径库 无法为“lib”分配绝对路径。 tar:./var/lib:无法创建目录:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径库 无法为“lib”分配绝对路径。 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径库 无法为“lib”分配绝对路径。 tar:./var/lib:无法创建目录:地址错误 tar:./var/lib/misc:无法创建目录:没有该文件或目录 获取到未知目录的 *at() 系统调用,文件描述符为 4 fd 4 的未知基路径,路径易失性 无法为“volatile”分配绝对路径。 tar:./var/volatile:无法创建目录:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 fd 4 的未知基路径,路径易失性 无法为“volatile”分配绝对路径。 获取到未知目录的 *at() 系统调用,文件描述符为 4 fd 4 的未知基路径,路径易失性 无法为“volatile”分配绝对路径。 tar:./var/volatile:无法创建目录:地址错误 tar:./var/volatile/tmp:无法创建目录:没有该文件或目录 获取到未知目录的 *at() 系统调用,文件描述符为 4 fd 4 的未知基路径,路径易失性 无法为“volatile”分配绝对路径。 获取到未知目录的 *at() 系统调用,文件描述符为 4 fd 4 的未知基路径,路径易失性 无法为“volatile”分配绝对路径。 tar:./var/volatile:无法创建目录:地址错误 tar:./var/volatile/log:无法创建目录:没有该文件或目录 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径日志 无法为“log”分配绝对路径。 tar:./var/log:无法创建指向“volatile/log”的符号链接:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的基本路径未知,路径锁定 无法为“lock”分配绝对路径。 tar:./var/lock:无法打开:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径假脱机 无法为“spool”分配绝对路径。 tar:./var/spool:无法创建目录:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 fd 4 的未知基本路径,路径备份 无法为“备份”分配绝对路径。 tar:./var/backups:无法创建目录:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 fd 4 的未知基本路径,路径运行 无法为“run”分配绝对路径。 tar:./var/run:无法打开:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径为 nsswitch.conf 无法为“nsswitch.conf”分配绝对路径。 tar:./etc/nsswitch.conf:无法打开:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 fd 4 的未知基本路径,路径 hosts 无法为“hosts”分配绝对路径。 tar:./etc/hosts:无法打开:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 fd 4 的未知基本路径,路径问题.net 无法为“issue.net”分配绝对路径。 tar:./etc/issue.net:无法打开:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 fd 4 的未知基本路径,路径配置文件 无法为“profile”分配绝对路径。 tar:./etc/profile:无法打开:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径默认值 无法为“default”分配绝对路径。 tar:./etc/default:无法创建目录:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的基本路径未知,路径问题 无法为“issue”分配绝对路径。 tar:./etc/issue:无法打开:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 fd 4 的未知基本路径,路径骨架 无法为“skel”分配绝对路径。 tar:./etc/skel:无法创建目录:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 fd 4 的未知基本路径,路径骨架 无法为“skel”分配绝对路径。 获取到未知目录的 *at() 系统调用,文件描述符为 4 fd 4 的未知基本路径,路径骨架 无法为“skel”分配绝对路径。 tar:./etc/skel:无法创建目录:地址错误 tar:./etc/skel/.profile:无法打开:没有该文件或目录 获取到未知目录的 *at() 系统调用,文件描述符为 4 fd 4 的未知基本路径,路径骨架 无法为“skel”分配绝对路径。 获取到未知目录的 *at() 系统调用,文件描述符为 4 fd 4 的未知基本路径,路径骨架 无法为“skel”分配绝对路径。 tar:./etc/skel:无法创建目录:地址错误 tar:./etc/skel/.bashrc:无法打开:没有该文件或目录 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径 mtab 无法为“mtab”分配绝对路径。 tar:./etc/mtab:无法打开:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的基本路径未知,路径主机名 无法为“hostname”分配绝对路径。 tar:./etc/hostname:无法打开:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 fd 4 的未知基本路径,路径 fstab 无法为“fstab”分配绝对路径。 tar:./etc/fstab:无法打开:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 fd 4 的未知基本路径,路径 shell 无法为“shells”分配绝对路径。 tar:./etc/shells:无法打开:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 文件描述符 4 的未知基本路径,路径 host.conf 无法为“host.conf”分配绝对路径。 tar:./etc/host.conf:无法打开:地址错误 获取到未知目录的 *at() 系统调用,文件描述符为 4 fd 4 的未知基础路径,路径 motd 无法为“motd”分配绝对路径。 tar:./etc/motd:无法打开:地址错误 tar:由于之前的错误,退出状态为失败。 错误:故障日志文件存储在:/home/vmc/Desktop/imx-yocto-bsp/build-wayland/tmp/work/imx8mqevk-poky-linux/base-files/3.0.14/temp/log.do_package.1734591 错误:任务 (/home/vmc/Desktop/imx-yocto-bsp/sources/poky/meta/recipes-core/base-files/base-files_3.0.14.bb:do_package) 执行失败,退出代码为“1” Re: base-files error when build the yocto linux 谢谢你。它已激活 Re: base-files error when build the yocto linux 在你的 Ubuntu 电脑上,运行命令“sudo apt install tar=1.34+dfsg-1build3”
View full article
如何为我们使用的 i.mx RT1062 路由器获取唯一的以太网 MAC 地址? 你好, 我们使用MIMXRT1062DVL6B,并通过以太网实现我们的产品。 首先,我们使用 `fsl_silicon_id.c` 中的 ` SILICONID_ConvertToMacAddr`为我们的产品实现 MAC 地址,以便使用 NXP 的 OUI 和硅 ID 为每个设备获取唯一的 MAC 地址。 但是,我们通过` SILICONID_ConvertToMacAddr`获取的 MAC 地址并不唯一,它们都相同。 我有个问题。 在调用 `SILICONID_ConvertToMacAddr` 之前,我们需要做哪些设置? 或者,`SILICONID_ConvertToMacAddr` 无法通过 NXP 设备获取唯一的 MAC 地址? 我们在 IMXRT1060RM.pdf 的 Rev. 4, 01/2026 中找不到答案。 您能给我们答案吗? 谢谢。 Re: How can I get unique ethernet MAC address all over the i.mx RT1062 we use? 嗨,阿布纳 感谢您的支持! 我们了解到,我们可以使用通过SILICONID_ConvertToMacAddr 函数获取的 MAC 地址作为我们产品的 MAC 地址。但我明白 SILICONID_ConvertToMacAddr 只是一个示例,我们不能将其用于我们的大规模产品。我们必须使用我们 OUI 下的 MAC 地址。 顺祝商祺! 茂 Re: How can I get unique ethernet MAC address all over the i.mx RT1062 we use? 嗨@shigeru-tsujita 感谢您发现这种情况。我们使用 SILICONID_ConvertToMacAddr 函数来减少 NXP MCUX SDK 示例中的 MAC 地址冲突,以用于我们的测试环境。我们在同一交换机上连接不同 SoC 的以太网接口。对于同一系列 SoC 的情况,我们可能无法涵盖。 但我不太明白的是,为什么你们要用这种方式生成产品 MAC 地址。首先,您的 OUI 应该使用您公司的 OUI。那么,我认为贵公司应该对唯一标识符有一个内部特殊定义。 Re: How can I get unique ethernet MAC address all over the i.mx RT1062 we use? 你好,梅。 我理解 SILICONID_ConvertToMacAddr 使用固定的 NXP OUI 和三个字节的硅 ID(它是 OCOTP->CFG0/1 的一部分)来生成 MAC 地址。 我观察了我们目标产品的 OCOTP->CFG0/1。 这些数值如下: - 一个 MIMXRT1062 - OCOTP->CFG0: (uint32_t)0x615c'faa4 - OCOTP->CFG1: (uint32_t)0x2a1e'61d7 - 其他 MIMXRT1062 - OCOTP->CFG0: (uint32_t)0x615c'faa4 - OCOTP->CFG1: (uint32_t)0x4922'61d7 因为 OCOTP->CFG0 的低三个字节在 SILICONID_ConvertToMacAddr 中用作 MAC 地址,所以它们的 MAC 地址相似。 因此,我们很多产品的 MAC 地址都很相似。(现在我们有几十个原型机,虽然我们不会检查所有的 MAC 地址,但我们还没有找到与 54:27:8D:A4:FA:5C 不同的 MAC 地址。) 谢谢。 Re: How can I get unique ethernet MAC address all over the i.mx RT1062 we use? 嗨@shigeru-tsujita , 非常感谢您对我们产品的关注以及对我们社区的使用。 假设 SDK 的 silicon_id 元器件已正确集成,则在调用 MIMXRT1062 的 SILICONID_ConvertToMacAddr() 之前无需进行其他设置。 请注意,SILICONID_ConvertToMacAddr() 不使用完整的 64 位硅 ID 来生成 MAC 地址。它使用固定的 NXP OUI 作为前 3 个字节,而最后 3 个字节仅使用来自硅 ID 的 3 个字节。 根据SDK代码: mayliu1_0-1783917944104.png 请您读取几个设备的 64 位硅唯一 ID,并检查 ID 值是否读取正确?另外,请比较 siliconId[0]、siliconId[1] 和 siliconId[2],因为这些是用于生成 MAC 地址的字节。 如果这三个字节在各个设备上都相同,则生成的 MAC 地址也将相同。 顺祝商祺! 5月 Re: How can I get unique ethernet MAC address all over the i.mx RT1062 we use? 这里的难点在于,由 OCOTP->CFG1 和 OCOTP->CFG0 形成的 64 位数据在芯片之间总是唯一的,但值之间可能只有几个比特的差异。所以,你必须找到一种方法将它们组合在一起,而不会丢失任何信息。我通过对 OCOTP->CFG1 和 OCOTP->CFG0 进行 CRC32 校验,然后使用该 32 位结果构建 MAC 地址,效果相当不错。 要实际生成 MAC 地址,您可以使用“本地管理”的 MAC 地址,其中包含两个常量字节和 32 位 CRC,或者使用您组织的 OUI 作为前三个字节,然后从 CRC 值中获取另外三个字节。
View full article
mc9s08qg8 code warrior (Classic IDE) v6.3 windows 11 I downloaded the file, but it will not install, the installer says my OS is wrong. I am using Windows 11 ? Re: mc9s08qg8 code warrior (Classic IDE) v6.3 windows 11 Hello, To use CodeWarrior in windows 11 please update to v11.1, I look for the MC9S08QG8 device and is available in this version. You can download from this link: CodeWarrior® for MCUs (Eclipse IDE)        11.1 Best Regards, Luis
View full article
SAF85xx HSE Update SMR Hi NXP,  Do we need to update SMR  when just only Signature bytes change due to code content change but code size, start address ,  key, pointer to signature ... are not changed ? Re: SAF85xx HSE Update SMR Hello, The SMR (Secure Memory Region) entry contains the metadata HSE uses to verify your application image. Even if: the size stays the same the start address stays the same the key handle stays the same the signature pointer stays the same …any modification to the code content produces a different signature, and HSE must verify the new signature. Because of this, the SMR entry that holds the signature must be rewritten with the updated signature bytes. The SMR entry is part of the authenticated boot chain; HSE cannot validate the updated binary unless its corresponding SMR entry reflects the new signature. FYI: Aptiv has direct NXP FAE, so feel free to get in touch with him for details. Best regards, Peter Re: SAF85xx HSE Update SMR Thank you for your response Re: SAF85xx HSE Update SMR Hi, How about in the case I flash new application + new signature (map with new application). in the case " code size, start address , key, pointer to signature" not change, do we need to re install SMR
View full article
Is i.MX 9 "there yet"? I started a project in a few years ago and NXP's i.MX 9 line of MPUs were beginning to be released but they were largely unobtainable so I went with a beefy i.MX 8. At this stage, it's way more power than I need and I'd like to move to a much smaller MPU. I was planning on getting the smallest i.MX 8 but the i.MX91 is the smallest cpu they have. I was wondering if I would be better off with the 91 instead of a more mature 8. Thermals are my primary concern so I would assume new is always better, but I just don't know if they are "there yet" since they are still fairly new. A more apples to apples port moving to an 8 could also be a motivator.
View full article
base-files error when build the yocto linux Build the yocto error. When i build and follow to guide of nxp by yocto. How to fix the error? WARNING: Logfile for failed setscene task is /home/vmc/Desktop/imx-yocto-bsp/build-wayland/tmp/work/armv8a-poky-linux/ptest-runner/2.4.5+git/temp/log.do_package_setscene.1680451 WARNING: Setscene task (/home/vmc/Desktop/imx-yocto-bsp/sources/poky/meta/recipes-support/ptest-runner/ptest-runner_2.4.5.bb:do_package_setscene) failed with exit code '1' - real task will be run instead ERROR: base-files-3.0.14-r0 do_package: Error executing a python function in exec_func_python() autogenerated: The stack trace of python calls that resulted in this exception/failure was: File: 'exec_func_python() autogenerated', lineno: 2, function: 0001: *** 0002:perform_packagecopy(d) 0003: File: '/home/vmc/Desktop/imx-yocto-bsp/sources/poky/meta/classes-global/package.bbclass', lineno: 363, function: perform_packagecopy 0359: rpath_replace (dvar, d) 0360:} 0361:perform_packagecopy[cleandirs] = "${PKGD}" 0362:perform_packagecopy[dirs] = "${PKGD}" *** 0363: 0364:python populate_packages () { 0365: oe.package.populate_packages(d) 0366:} 0367:populate_packages[dirs] = "${D}" File: '/usr/lib/python3.10/subprocess.py', lineno: 421, function: check_output 0417: else: 0418: empty = b'' 0419: kwargs['input'] = empty 0420: *** 0421: return run(*popenargs, stdout=PIPE, timeout=timeout, check=True, 0422: **kwargs).stdout 0423: 0424: 0425:class CompletedProcess(object): File: '/usr/lib/python3.10/subprocess.py', lineno: 526, function: run 0522: # We don't call process.wait() as .__exit__ does that for us. 0523: raise 0524: retcode = process.poll() 0525: if check and retcode: *** 0526: raise CalledProcessError(retcode, process.args, 0527: output=stdout, stderr=stderr) 0528: return CompletedProcess(process.args, retcode, stdout, stderr) 0529: 0530: Exception: subprocess.CalledProcessError: Command 'tar --exclude=./sysroot-only -cf - -C /home/vmc/Desktop/imx-yocto-bsp/build-wayland/tmp/work/imx8mqevk-poky-linux/base-files/3.0.14/image -p -S . | tar -xf - -C /home/vmc/Desktop/imx-yocto-bsp/build-wayland/tmp/work/imx8mqevk-poky-linux/base-files/3.0.14/package' returned non-zero exit status 2. Subprocess output: got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path bin couldn't allocate absolute path for 'bin'. tar: ./usr/bin: Cannot mkdir: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path lib couldn't allocate absolute path for 'lib'. tar: ./usr/lib: Cannot mkdir: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path games couldn't allocate absolute path for 'games'. tar: ./usr/games: Cannot mkdir: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path share couldn't allocate absolute path for 'share'. tar: ./usr/share: Cannot mkdir: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path share couldn't allocate absolute path for 'share'. got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path share couldn't allocate absolute path for 'share'. tar: ./usr/share: Cannot mkdir: Bad address tar: ./usr/share/dict: Cannot mkdir: No such file or directory got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path share couldn't allocate absolute path for 'share'. got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path share couldn't allocate absolute path for 'share'. tar: ./usr/share: Cannot mkdir: Bad address tar: ./usr/share/man: Cannot mkdir: No such file or directory got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path share couldn't allocate absolute path for 'share'. got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path share couldn't allocate absolute path for 'share'. tar: ./usr/share: Cannot mkdir: Bad address tar: ./usr/share/doc: Cannot mkdir: No such file or directory got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path share couldn't allocate absolute path for 'share'. got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path share couldn't allocate absolute path for 'share'. tar: ./usr/share: Cannot mkdir: Bad address tar: ./usr/share/doc/base-files-3.0.14: Cannot mkdir: No such file or directory got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path share couldn't allocate absolute path for 'share'. got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path share couldn't allocate absolute path for 'share'. tar: ./usr/share: Cannot mkdir: Bad address tar: ./usr/share/misc: Cannot mkdir: No such file or directory got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path share couldn't allocate absolute path for 'share'. got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path share couldn't allocate absolute path for 'share'. tar: ./usr/share: Cannot mkdir: Bad address tar: ./usr/share/common-licenses: Cannot mkdir: No such file or directory got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path share couldn't allocate absolute path for 'share'. got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path share couldn't allocate absolute path for 'share'. tar: ./usr/share: Cannot mkdir: Bad address tar: ./usr/share/info: Cannot mkdir: No such file or directory got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path sbin couldn't allocate absolute path for 'sbin'. tar: ./usr/sbin: Cannot mkdir: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path src couldn't allocate absolute path for 'src'. tar: ./usr/src: Cannot mkdir: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path include couldn't allocate absolute path for 'include'. tar: ./usr/include: Cannot mkdir: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path tmp couldn't allocate absolute path for 'tmp'. tar: ./var/tmp: Cannot create symlink to ‘volatile/tmp’: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path local couldn't allocate absolute path for 'local'. tar: ./var/local: Cannot mkdir: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path lib couldn't allocate absolute path for 'lib'. tar: ./var/lib: Cannot mkdir: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path lib couldn't allocate absolute path for 'lib'. got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path lib couldn't allocate absolute path for 'lib'. tar: ./var/lib: Cannot mkdir: Bad address tar: ./var/lib/misc: Cannot mkdir: No such file or directory got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path volatile couldn't allocate absolute path for 'volatile'. tar: ./var/volatile: Cannot mkdir: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path volatile couldn't allocate absolute path for 'volatile'. got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path volatile couldn't allocate absolute path for 'volatile'. tar: ./var/volatile: Cannot mkdir: Bad address tar: ./var/volatile/tmp: Cannot mkdir: No such file or directory got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path volatile couldn't allocate absolute path for 'volatile'. got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path volatile couldn't allocate absolute path for 'volatile'. tar: ./var/volatile: Cannot mkdir: Bad address tar: ./var/volatile/log: Cannot mkdir: No such file or directory got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path log couldn't allocate absolute path for 'log'. tar: ./var/log: Cannot create symlink to ‘volatile/log’: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path lock couldn't allocate absolute path for 'lock'. tar: ./var/lock: Cannot open: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path spool couldn't allocate absolute path for 'spool'. tar: ./var/spool: Cannot mkdir: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path backups couldn't allocate absolute path for 'backups'. tar: ./var/backups: Cannot mkdir: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path run couldn't allocate absolute path for 'run'. tar: ./var/run: Cannot open: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path nsswitch.conf couldn't allocate absolute path for 'nsswitch.conf'. tar: ./etc/nsswitch.conf: Cannot open: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path hosts couldn't allocate absolute path for 'hosts'. tar: ./etc/hosts: Cannot open: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path issue.net couldn't allocate absolute path for 'issue.net'. tar: ./etc/issue.net: Cannot open: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path profile couldn't allocate absolute path for 'profile'. tar: ./etc/profile: Cannot open: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path default couldn't allocate absolute path for 'default'. tar: ./etc/default: Cannot mkdir: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path issue couldn't allocate absolute path for 'issue'. tar: ./etc/issue: Cannot open: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path skel couldn't allocate absolute path for 'skel'. tar: ./etc/skel: Cannot mkdir: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path skel couldn't allocate absolute path for 'skel'. got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path skel couldn't allocate absolute path for 'skel'. tar: ./etc/skel: Cannot mkdir: Bad address tar: ./etc/skel/.profile: Cannot open: No such file or directory got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path skel couldn't allocate absolute path for 'skel'. got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path skel couldn't allocate absolute path for 'skel'. tar: ./etc/skel: Cannot mkdir: Bad address tar: ./etc/skel/.bashrc: Cannot open: No such file or directory got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path mtab couldn't allocate absolute path for 'mtab'. tar: ./etc/mtab: Cannot open: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path hostname couldn't allocate absolute path for 'hostname'. tar: ./etc/hostname: Cannot open: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path fstab couldn't allocate absolute path for 'fstab'. tar: ./etc/fstab: Cannot open: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path shells couldn't allocate absolute path for 'shells'. tar: ./etc/shells: Cannot open: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path host.conf couldn't allocate absolute path for 'host.conf'. tar: ./etc/host.conf: Cannot open: Bad address got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path motd couldn't allocate absolute path for 'motd'. tar: ./etc/motd: Cannot open: Bad address tar: Exiting with failure status due to previous errors ERROR: Logfile of failure stored in: /home/vmc/Desktop/imx-yocto-bsp/build-wayland/tmp/work/imx8mqevk-poky-linux/base-files/3.0.14/temp/log.do_package.1734591 ERROR: Task (/home/vmc/Desktop/imx-yocto-bsp/sources/poky/meta/recipes-core/base-files/base-files_3.0.14.bb:do_package) failed with exit code '1' Re: base-files error when build the yocto linux Thanks u. It actived Re: base-files error when build the yocto linux On your ubuntu PC, run the command "sudo apt install tar=1.34+dfsg-1build3"
View full article
How can I get unique ethernet MAC address all over the i.mx RT1062 we use? Hi,  We use MIMXRT1062DVL6B and realize our product with ethernet. First, we implement the MAC address for our product using `SILICONID_ConvertToMacAddr` on `fsl_silicon_id.c` to get unique MAC address per device with NXP's OUI and silicon ID. But the MAC address we got via `SILICONID_ConvertToMacAddr` was not unique, and they were all identical. So, I have a question. Do we have any setting before calling `SILICONID_ConvertToMacAddr`? Or, `SILICONID_ConvertToMacAddr` does not work to get unique MAC address over the NXP device? We couldn't find answer in IMXRT1060RM.pdf of Rev. 4, 01/2026. Could you give us the answer? thank you. Re: How can I get unique ethernet MAC address all over the i.mx RT1062 we use? Hi, Abner Thank you for your supporting,  We understood that we can use MAC address got via SILICONID_ConvertToMacAddr for our product. But I understand SILICONID_ConvertToMacAddr is just an example and we can't use it for our mass product. And we have to use the MAC address under our OUI. Best regards. Shigeru Re: How can I get unique ethernet MAC address all over the i.mx RT1062 we use? Hi @shigeru-tsujita  Thanks to find this situation. SILICONID_ConvertToMacAddr is used for NXP MCUX SDK example to reduce MAC address conflict in our test environment. We connect to different Socs' eth in same switch. For this same series Soc situation, we may not cover. But what I'm confused is why you use this way to generate your product MAC address. First of all, your OUI should use your company's one. Then the unique ID I think your company should have a internal special definition. Re: How can I get unique ethernet MAC address all over the i.mx RT1062 we use? Hi, May. I understand SILICONID_ConvertToMacAddr make MAC address using fixed NXP OUI and three bytes of silicon ID(it's part of OCOTP->CFG0/1). I observed the OCOTP->CFG0/1 of our target product. Those values are following: - one MIMXRT1062   - OCOTP->CFG0: (uint32_t)0x615c'faa4   - OCOTP->CFG1: (uint32_t)0x2a1e'61d7 - other MIMXRT1062   - OCOTP->CFG0: (uint32_t)0x615c'faa4   - OCOTP->CFG1: (uint32_t)0x4922'61d7 Because lower three bytes of OCOTP->CFG0 is used for MAC address in SILICONID_ConvertToMacAddr, they have similar MAC address. So, many of our product have similar MAC address. (Now we have handreds of prototype and we don't check all MAC address, but we couldn't find differnt MAC address with 54:27:8D:A4:FA:5C yet.) thank you. Re: How can I get unique ethernet MAC address all over the i.mx RT1062 we use? Hi @shigeru-tsujita, Thank you so much for your interest in our products and for using our community. Assuming the SDK silicon_id component is correctly integrated, no additional setting is required before calling SILICONID_ConvertToMacAddr() for MIMXRT1062. Please note that SILICONID_ConvertToMacAddr() does not use the full 64-bit silicon ID to generate the MAC address. It uses a fixed NXP OUI for the first 3 bytes and only 3 bytes from the silicon ID for the last 3 bytes. According to the SDK code: mayliu1_0-1783917944104.png Could you please read the 64-bit silicon unique ID from several devices and check whether the ID values are read correctly? Please also compare siliconId[0] , siliconId[1] , and siliconId[2] , as these are the bytes used to generate the MAC address. If these three bytes are identical across devices, the generated MAC addresses will also be identical. Best Regards May Re: How can I get unique ethernet MAC address all over the i.mx RT1062 we use? The difficult part here is that the 64-bit data formed by OCOTP->CFG1 and OCOTP->CFG0 will always be unique from chip to chip, but there may only be a few bits' difference between the values. So, you have to find a way to combine them together in a way that doesn't lose any information. I have had pretty good luck with doing this by taking a CRC32 of OCOTP->CFG1 and OCOTP->CFG0, then using that 32-bit result to build the MAC address. To actually generate the MAC, you could use a "locally administered" MAC address with two constant bytes then the 32-bit CRC, or use your organization's OUI for the first three bytes, then take the other three bytes from the CRC value. 
View full article
i.MX95 EVKベースボード設計に関する疑問 mrnobody_0-1784709346702.png これはIMX95ボードに12Vの電源入力がどのように取り込まれるかの回路図です。この設計には少し疑問があります... 1. なぜ20Aのヒューズが2本並列に接続されているのか、40Aの定格電流で行われているのか、それは良い方法なのか? 2. Q2が「オン」のとき、Q2のゲートはGNDに接続されますが、Q2を「オフ」にする際はゲートは浮遊状態のままになります。これは信頼できるのでしょうか?ゲートピンはソース電圧までプルアップすべきでしょうか? Re: Doubt regarding i.MX95 EVK base board design 40Aのヒューズを使わないのはなぜですか?サイズ制限のためですか? Re: Doubt regarding i.MX95 EVK base board design Q1。突入電流が20Aを超えるため、20A定格のヒューズを2枚(小型サイズ1206)で使用し、コスト効率の高い電流定格を提供するのが良い方法です。 Q2.Q2がオフのとき、そのゲートピンは浮かんだままではなく、100Khmsの抵抗(R197)でソースピンと同じ電源レールに引き上げられ、完全にオフにできます。 Re: Doubt regarding i.MX95 EVK base board design もし40A定格の小型ヒューズを調達できれば、20Aの20Aヒューズをそれに交換できるでしょう。ヒューズ保護が不要な場合は、ヒューズもショートさせることができます。
View full article
私たちが使っている i.mx RT1062全体でイーサネットMACアドレスを一意に取得するにはどうすればいいですか? こんにちは、 私たちは イーサネットでMIMXRT1062DVL6Bし、製品を実現させてください。 まず、製品のMACアドレスを「SILICONID_ConvertToMacAddr」で実装します。「fsl_silicon_id.c」上で、NXPのOUIとシリコンIDを持つデバイスごとのユニークなMACアドレスを取得するために。 でもMACアドレスは SILICONID_ConvertToMacAddrは唯一無二ではなく、すべて同一だった。 質問があります。 「SILICONID_ConvertToMacAddr」と呼ぶ前に何か設定はありますか? それとも、「SILICONID_ConvertToMacAddr」はNXPデバイス上で一意のMACアドレスを取得するために機能しませんか? 2026年1月4号のIMXRT1060RM.pdfでは答えが見つかりませんでした。 答えを教えていただけますか? ありがとうございます。 Re: How can I get unique ethernet MAC address all over the i.mx RT1062 we use? やあ、アブナー ご支援ありがとうございます。 MACアドレスを使えることは理解しましたSILICONID_ConvertToMacAddr製品に。しかし、SILICONID_ConvertToMacAddrはあくまで例であり、大量生産には使えないと理解しています。そして、OUIのMACアドレスを使わなければなりません。 よろしくお願いいたします。 茂 Re: How can I get unique ethernet MAC address all over the i.mx RT1062 we use? こんにちは、@shigeru辻田  この状況を見つけてくれてありがとうございます。SILICONID_ConvertToMacAddrはNXP MCUX SDKの例として、テスト環境でのMACアドレスの競合を減らすために使われています。同じスイッチで異なるSocsのETHに接続しています。同じシリーズのSocの状況については、ここでは触れないかもしれません。 しかし、なぜこの方法で製品のMACアドレスを生成するのかが混乱しています。まず第一に、あなたのOUIは会社のものを使うべきです。そして、ユニークIDについては、会社内に特別な定義があるはずです。 Re: How can I get unique ethernet MAC address all over the i.mx RT1062 we use? こんにちは、メイ。 SILICONID_ConvertToMacAddrは、固定のNXP OUIと3バイトのシリコンID(OCOTP->CFG0/1の一部)を使用してMACアドレスを生成すると理解しています。 ターゲット製品のOCOTP->CFG0/1を観察しました。 それらの値は以下のとおりです。 - MIMXRT1062 1個 - OCOTP->CFG0: (uint32_t)0x615c'faa4 - OCOTP->CFG1: (uint32_t)0x2a1e'61d7 - その他のMIMXRT1062 - OCOTP->CFG0: (uint32_t)0x615c'faa4 - OCOTP->CFG1: (uint32_t)0x4922'61d7 OCOTP->CFG0 の下位 3 バイトが SILICONID_ConvertToMacAddr の MAC アドレスに使用されるため、両者の MAC アドレスは類似しています。 SO、多くの製品は似たMACアドレスを持っています。(現在、数百個のプロトタイプを保有しており、すべてのMACアドレスをチェックしているわけではありませんが、54:27:8D:A4:FA:5Cとは異なるMACアドレスはまだ見つかっていません。) ありがとう。 Re: How can I get unique ethernet MAC address all over the i.mx RT1062 we use? こんにちは@shigeru-tsujitaさん 私たちの製品にご関心を寄せ、コミュニティをご利用いただき、本当にありがとうございます。 SDK silicon_idコンポーネントが正しく統合されていると仮定すれば、MIMXRT1062のためにSILICONID_ConvertToMacAddr()を呼び出す前に追加の設定は必要ありません。 SILICONID_ConvertToMacAddr() は、MAC アドレスを生成する際に、完全な 64 ビットのシリコン ID を使用しないことにご注意ください。最初の3バイトには固定のNXP OUIを使用し、最後の3バイトにはシリコンIDから3バイトのみを使用します。 SDKコードによると: mayliu1_0-1783917944104.png 複数のデバイスから64ビットシリコンのユニークIDを読み取り、ID値が正しく読み取られているか確認してもらえますか?また、siliconId[0]、siliconId[1]、siliconId[2]も比較してください。これらはMACアドレスを生成するために使用されるバイトです。 これらの3バイトがデバイス間で同一であれば、生成されるMACアドレスも同一になります。 よろしくお願いいたします。 5月 Re: How can I get unique ethernet MAC address all over the i.mx RT1062 we use? ここで難しいのは、OCOTP->CFG1とOCOTP->CFG0によって形成される64ビットデータはチップごとに常に一意であるにもかかわらず、値の違いはわずか数ビットしかない場合があることです。だからこそ、情報を失わないようにそれらを組み合わせる方法を見つけなければなりません。私は、OCOTP->CFG1とOCOTP->CFG0のCRC32を取得し、その32ビットの結果を使用してMACアドレスを構築することで、かなりうまくいっています。 実際にMACを生成するには、「ローカル管理」MACアドレス(定数2バイトの後に32ビットCRC)を使うか、組織のOUIを最初の3バイトに使い、残りの3バイトをCRCの値から取る方法もあります。
View full article
Yocto Linuxをビルドする際のbase-filesエラー Build the Yoctoエラー。私が作ったときは、YoctoのNXPガイドに従っています。エラーを修正するにはどうすればよいですか? 警告:失敗したセットシーンタスクのログファイルは /home/vmc/Desktop/imx-yocto-bsp/build-wayland/tmp/work/armv8a-poky-Linux/ptest-runner/2.4.5+git/temp/log.do_package_setscene.1680451 です。 警告:セットシーンタスク(/home/vmc/Desktop/imx-Yocto-bsp/sources/poky/meta/recipes-サポート/ptest-runner/ptest-runner_2.4.5.bb:do_package_setscene)が終了コード「1」で失敗しました。代わりに実際のタスクが実行されます エラー:base-files-3.0.14-r0 do_package:exec_func_python()でPython関数を実行する際にエラーが発生します。 この例外/失敗を引き起こしたPython呼び出しのスタックトレースは以下の通りです: ファイル: 'exec_func_python() autogenerated', lineno: 2, function: 0001: 0002:perform_packagecopy(d) 0003: ファイル: '/ホーム/vmc/Desktop/imx-Yocto-bsp/sources/poky/meta/classes-global/package.bbclass', lineno: 363, function: perform_packagecopy 0359: rpath_replace (dvar, d) 0360:} 0361:perform_packagecopy[cleandirs] = "${PKGD}" 0362:perform_packagecopy[指揮] = "${PKGD}" *** 0363: 0364:Python populate_パッケージs () { 0365: oe.package.populate_パッケージs(d) 0366:} 0367:populate_packages[dirs] = " ${D} " ファイル: '/usr/lib/python3.10/subprocess.py'、行番号: 421、関数: check_output 0417: それ以外の場合: 0418: 空 = b'' 0419: kwargs['input'] = 空 0420: *** 0421: return run(*popenargs, stdout=PIPE, timeout=timeout, check=True, 0422: **kwargs).stdout 0423: 0424: 0425:class CompletedProcess(object): ファイル: '/usr/lib/python3.10/subprocess.py'、行番号: 526、関数: 実行 0522: # process.wait() は呼び出しませんとして。 __exit__それは私たちのためにやってくれる。 0523: 上げる 0524: retcode = process.poll() 0525: チェックして戻りコードを取得する場合: *** 0526: raise CalledProcessError(retcode, process.args, 0527: 出力=標準出力、標準エラー=標準エラー) 0528: return CompletedProcess(process.args, retcode, stdout, stderr) 0529: 0530: 例外: subprocess.CalledProcessError: コマンド 'tar --exclude=./sysroot-only'-cf - -C /home/vmc/Desktop/imx-yocto-bsp/build-wayland/tmp/work/imx8mqevk-poky-linux/base-files/3.0.14/image -p -S .|tar -xf - -C /home/vmc/Desktop/imx-yocto-bsp/build-wayland/tmp/work/imx8mqevk-poky-linux/base-files/3.0.14/package' は終了ステータス2を返しました。 サブプロセスの出力: 不明なディレクトリ、fd 4 に対して *at() システムコールが呼び出されました fd 4 の不明なベースパス、パス bin 'bin' の絶対パスを割り当てられませんでした。 tar: ./usr/bin:Cannot mkdir: 悪いアドレス 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知の基底パス、パスライブラリ 「リベラル」に絶対的な道を割り当てることができませんでした。 tar: ./usr/lib:Cannot mkdir: 悪いアドレス 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、Path Games 『ゲーム』に絶対的な道を割り当てることができませんでした。 tar: ./usr/games:Cannot mkdir: 悪いアドレス 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パス共有 「シェア」の絶対的な経路を割り当てることができませんでした。 tar: ./usr/share:Cannot mkdir: 悪いアドレス 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パス共有 「シェア」の絶対的な経路を割り当てることができませんでした。 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パス共有 「シェア」の絶対的な経路を割り当てることができませんでした。 tar: ./usr/share:Cannot mkdir: 悪いアドレス TAR: ./USR/Share/DICT:Cannot mkdir:そのようなファイルやディレクトリは存在しません 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パス共有 「シェア」の絶対的な経路を割り当てることができませんでした。 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パス共有 「シェア」の絶対的な経路を割り当てることができませんでした。 tar: ./usr/share:Cannot mkdir: 悪いアドレス タール:./USR/シェア/男:Cannot mkdir:そのようなファイルやディレクトリは存在しません 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パス共有 「シェア」の絶対的な経路を割り当てることができませんでした。 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パス共有 「シェア」の絶対的な経路を割り当てることができませんでした。 tar: ./usr/share:Cannot mkdir: 悪いアドレス tar: ./usr/share/doc:Cannot mkdir:そのようなファイルやディレクトリは存在しません 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パス共有 「シェア」の絶対的な経路を割り当てることができませんでした。 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パス共有 「シェア」の絶対的な経路を割り当てることができませんでした。 tar: ./usr/share:Cannot mkdir: 悪いアドレス tar: ./usr/share/doc/base-files-3.0.14:Cannot mkdir:そのようなファイルやディレクトリは存在しません 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パス共有 「シェア」の絶対的な経路を割り当てることができませんでした。 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パス共有 「シェア」の絶対的な経路を割り当てることができませんでした。 tar: ./usr/share:Cannot mkdir: 悪いアドレス TAR: ./USR/Share/MISC:Cannot mkdir:そのようなファイルやディレクトリは存在しません 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パス共有 「シェア」の絶対的な経路を割り当てることができませんでした。 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パス共有 「シェア」の絶対的な経路を割り当てることができませんでした。 tar: ./usr/share:Cannot mkdir: 悪いアドレス TAR: ./USR/share/common-licenses:Cannot mkdir:そのようなファイルやディレクトリは存在しません 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パス共有 「シェア」の絶対的な経路を割り当てることができませんでした。 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パス共有 「シェア」の絶対的な経路を割り当てることができませんでした。 tar: ./usr/share:Cannot mkdir: 悪いアドレス tar: ./usr/share/info:Cannot mkdir:そのようなファイルやディレクトリは存在しません 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知の基底パス、パスSBIN 「sbin」に絶対的な経路を割り当てることができませんでした。 tar: ./usr/sbin:Cannot mkdir: 悪いアドレス 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パスSRC 「SRC」に絶対的な経路を割り当てることができませんでした。 tar: ./usr/src:Cannot mkdir: 悪いアドレス 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知の基線経路、経路には以下が含まれます 「インクルーク」の絶対的な経路を割り当てることができませんでした。 tar: ./usr/include:Cannot mkdir: 悪いアドレス 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知の基底経路、経路TMP 「TMP」の絶対経路を割り当てられませんでした。 tar: ./var/tmp:「volatile/tmp」へのシンプレリックリンクを作成できません:アドレスが悪い 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パスローカル 「ローカル」に絶対的な経路を割り当てることができませんでした。 tar: ./var/local:Cannot mkdir: 悪いアドレス 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知の基底パス、パスライブラリ 「リベラル」に絶対的な道を割り当てることができませんでした。 tar: ./var/lib:Cannot mkdir: 悪いアドレス 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知の基底パス、パスライブラリ 「リベラル」に絶対的な道を割り当てることができませんでした。 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知の基底パス、パスライブラリ 「リベラル」に絶対的な道を割り当てることができませんでした。 tar: ./var/lib:Cannot mkdir: 悪いアドレス tar: ./var/lib/misc:Cannot mkdir:そのようなファイルやディレクトリは存在しません 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パスボラタイル 「不安定」に絶対的な経路を割り当てることができなかった。 tar: ./var/volatile:Cannot mkdir: 悪いアドレス 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パスボラタイル 「不安定」に絶対的な経路を割り当てることができなかった。 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パスボラタイル 「不安定」に絶対的な経路を割り当てることができなかった。 tar: ./var/volatile:Cannot mkdir: 悪いアドレス TAR:./VAR/Volatile/TMP:Cannot mkdir:そのようなファイルやディレクトリは存在しません 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パスボラタイル 「不安定」に絶対的な経路を割り当てることができなかった。 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パスボラタイル 「不安定」に絶対的な経路を割り当てることができなかった。 tar: ./var/volatile:Cannot mkdir: 悪いアドレス タール:./VAR/揮発性/ログ:Cannot mkdir:そのようなファイルやディレクトリは存在しません 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知の基線経路、経路記録 「log」に絶対パスを割り当てることができませんでした。 tar: ./var/log:'volatile/log'へのシンモリンクを作成できません:アドレスが悪い 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パスロック 「ロック」の絶対経路を割り当てることができませんでした。 tar: ./var/lock:開けられない:住所が悪い 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知の基底経路、経路スプール 「スプール」の絶対経路を割り当てられませんでした。 tar: ./var/spool:Cannot mkdir: 悪いアドレス 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知の基地経路、経路バックアップ 「バックアップ」に絶対的な経路を割り当てることができませんでした。 tar: ./var/backups:Cannot mkdir: 悪いアドレス 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知の基地経路、経路走行 「走る」ための絶対的な経路を割り当てられなかった。 tar: ./var/run:開けられない:住所が悪い 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パスNSswitch.conf 'nsswitch.conf' の絶対パスを割り当てられませんでした。 tar: ./etc/nsswitch.conf:開けられない:住所が悪い 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パスホスト 「ホスト」に絶対的な経路を割り当てることができませんでした。 tar: ./etc/hosts:開けられない:住所が悪い 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知の基地経路、経路 issue.net 'issue.net' の絶対パスを割り当てられませんでした。 tar: ./etc/issue.net:開けられない:住所が悪い 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知の基線パス、パスプロファイル 「プロファイル」の絶対パスを割り当てられませんでした。 tar: ./etc/profile:開けられない:住所が悪い 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パスデフォルト 「デフォルト」の絶対パスを割り当てられませんでした。 tar: ./etc/default:Cannot mkdir: 悪いアドレス 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パスの問題 「問題」の絶対的な経路を割り当てることができませんでした。 tar: ./etc/issue:開けられない:住所が悪い 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パススケル 「スケル」に絶対的な経路を割り当てることができませんでした。 tar: ./etc/skel:Cannot mkdir: 悪いアドレス 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パススケル 「スケル」に絶対的な経路を割り当てることができませんでした。 不明なディレクトリ、fd 4 に対して *at() システムコールが呼び出されました fd 4 の不明なベースパス、パススケルトン 'skel' の絶対パスを割り当てられませんでした。 tar: ./etc/skel:Cannot mkdir: 悪いアドレス tar: ./etc/skel/.profile:開けられない:そのようなファイルやディレクトリは存在しません 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パススケル 「スケル」に絶対的な経路を割り当てることができませんでした。 不明なディレクトリ、fd 4 に対して *at() システムコールが呼び出されました fd 4 の不明なベースパス、パススケルトン 'skel' の絶対パスを割り当てられませんでした。 tar: ./etc/skel:Cannot mkdir: 悪いアドレス tar: ./etc/skel/.bashrc:開けられない:そのようなファイルやディレクトリは存在しません 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パスMTAB 「MTAB」の絶対経路を割り当てることができませんでした。 tar: ./etc/mtab:開けられない:住所が悪い 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パスホスト名 「ホスト名」に絶対パスを割り当てられませんでした。 tar: ./etc/hostname:開けられない:住所が悪い 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パスFSTAB 「FSTAB」の絶対パスを割り当てることができませんでした。 tar: ./etc/fstab:開けられない:住所が悪い 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知の基底経路、パスシェル 「砲弾」に絶対経路を割り当てることができませんでした。 tar: ./etc/shells:開けられない:住所が悪い 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知のベースパス、パスhost.conf 'host.conf' の絶対パスを割り当てられませんでした。 tar: ./etc/host.conf: 開けられない: アドレスが悪い 未知ディレクトリの*at() syscallを取得、fd 4 FD 4の未知の基道、パスMODT 『MODD』の絶対的な経路を割り当てることができませんでした。 tar: ./etc/motd:開けられない:住所が悪い tar:過去のエラーにより故障状態で退出 エラー:失敗ログファイルは以下のフォルダに保存されています:/home/vmc/Desktop/imx-yocto-bsp/build-wayland/tmp/work/imx8mqevk-poky-linux/base-files/3.0.14/temp/log.do_package.1734591 エラー:タスク(/ホーム/vmc/Desktop/imx-yocto-bsp/sources/poky/meta/recipes-core/base-files/base-files_3.0.14.bb:do_package)が終了コード「1」で失敗しました Re: base-files error when build the yocto linux ありがとう。起動しました Re: base-files error when build the yocto linux Ubuntu PCで、「sudo apt install tar=1.34+dfsg-1build3」コマンドを実行してください。
View full article
对 i.MX95 EVK 底板设计存在疑问 mrnobody_0-1784709346702.png 这是imx95板12V电源输入的原理图,我对这个设计有一些疑问…… 1. 为什么两个 20A 的熔丝要并联?是为了达到 40A 的额定电流吗?这样做是好的做法吗? 2. 当 Q2 处于“开”状态时,Q2 的栅极连接到 GND;但当 Q2 处于“关”状态时,栅极处于浮空状态。这样做可靠吗?是否应该将栅极引脚上拉至源极电压? Re: Doubt regarding i.MX95 EVK base board design 为什么不使用40A的熔丝?是因为尺寸限制吗? Re: Doubt regarding i.MX95 EVK base board design Q1. 由于浪涌电流大于 20A,因此使用 2 个额定电流为 20A 的小尺寸(1206)熔丝来提供更高的电流额定值是一种经济有效的好做法。 Q2.当 Q2 关闭时,其栅极引脚不会浮空,而是通过 100K 欧姆电阻 (R197) 上拉至与其源极引脚相同的电源轨,以便将其完全关闭。 Re: Doubt regarding i.MX95 EVK base board design 如果能找到额定电流为 40A 的小尺寸熔丝,就可以用它替换掉原来的 2 个 20A 熔丝。如果不需要熔丝保护,也可以将熔丝短路。
View full article
Doubt regarding i.MX95 EVK base board design mrnobody_0-1784709346702.png This is the schematic of how 12v power input is taken into the imx95 board, i have some doubts regarding this design... 1. why are 2 fuses of 20A connected in parallel, is it done for 40A current rating, is it a good practice to do so? 2. When Q2 is "on" the gate of Q2 is connected to GND, but for turning "off" Q2, the gate is just left in floating state, Is it reliable to do so? should the gate pin be pulled up to source voltage? Re: Doubt regarding i.MX95 EVK base board design why not use a 40A fuse, is it bcos of size constrains Re: Doubt regarding i.MX95 EVK base board design Q1. Since the inrush current is higher than 20A, it is a good practice to use 2 pcs of fuses with 20A rating in small size (1206) to provide higher current rating cost-effectively. Q2. When Q2 is off, its Gate pin is not left floating, but pulled up to the same power rail as its Source pin with 100KOhms resistor (R197) so that it can be turned off completely. Re: Doubt regarding i.MX95 EVK base board design If 40A rating small size fuse could be be sourced, the  2pcs 20A fuses could be replaced with it. If fuse protection is not necessary, the fuses can be shorted as well.
View full article
PN7160A 和 linux_libnfc-nci 在 Raspberry Pi 5 2026 64 位 Trixie 系统上运行 你好, 我正在尝试为工作项目启动 PN7160A,但始终无法让 linux_libnfc-nci 正常工作。该补丁已过时,lgpiod 在版本 2 中进行了全面改进。 还需要使用标志 sudo make install CFLAGS="-Wno-error=implicit-function-declaration" " 否则我就会 "demoapp/main.c:在函数“onMessageReceived”中: demoapp/main.c:451:5:错误:隐式声明函数“PrintNDEFContent” [-Wimplicit-function-declaration] 451 | PrintNDEFContent(NULL, NULL, message, length); 我找到了 2025 年关于 PN7150 的一篇旧帖子,但是当我尝试编译时,我遇到了奇怪的错误,例如“uint8_t”未在作用域中声明,请使用 。我的树莓派操作系统是最新的Trixie Debian 13.6。 需要一些帮助,谢谢。 Re: PN7160A and linux_libnfc-nci on Raspberry Pi 5 2026 64-bit Trixie 你好@paulwitulski 请将补丁作为附件应用。
View full article
NXP iMX8MP: U-Boot内のWFIベースのCPUアイドル状態が復帰しない 親愛なるNXPサポートチームへ、 私たちはi.MX8M Plusベースの製品向けにU-Bootの低消費電力待機メカニズムを調査しており、NXPからの指導を歓迎する段階に達しています。 ソフトウェアのバージョン SoC: NXP i.MX8M Plus BSP: ATF: lf_v2.10_android-15.0.0_1.2.0 U-Boot: lf_v2024.04_android-15.0.0_1.2.0 公開されているNXP BSPに基づいています(Varisciteフォークには、ATF/GICコードパスに関する重要な変更は含まれていません)。 ゴール アプリはAndroidを起動する前に、バッテリーが完全に放電された状態で数分間U-Bootに留まっている必要があります。 mdelay()に基づくビジーループは不必要な電力を消費し、追加の熱を発生させるため、ARMジェネリックタイマー(CNTP, PPI 30)を使って定期的に低消費電力のアイドル状態とウェイクに入ろうとしています。 初期実装 CNTPタイマーの設定 PPI 30を有効にする EL2から生のwfi()を実行する プロセッサはwfi()から決して起動しません。UARTの出力は、例外やクラッシュもなく、単に停止するだけです。 PSCIの実装 PSCI_VERSIONは1.1を返します。 PSCI_FEATURES(CPU_SUSPEND) は 0 を返します (サポートされています) CPU_SUSPENDを呼び出してスタンバイ電源状態を要求します これにより、ATFスタンバイ実装であるimx_cpu_standby()に到達しますが、システムは全く同じようにハングアップします。例外も発生せず、UART出力もなく、実行は再開されません。 したがって、両方とも: EL2で実行されたraw wfi() wfi() は ATF を介して PSCI で実行されます 全く同じ動作を生み出す。 既に検証済みのもの CPUとタイマー U-BootはEL2上で実行されます。 CNTPタイマーは正しくプログラムされています。 CNTP_TVAL_EL0 は正しくカウントダウンします。 CNTP_CTL_EL0 には以下が表示されます。 有効 = 1 IMASK = 0 武装直後のISTATUSは0です。 CPUインターフェース ICC_PMR_EL1は正しく設定されています。 ICC_IGRPEN1_EL1が有効になっています。 仮想化 HCR_EL2には以下が含まれます: IMO = 0 FMO = 0 したがって、EL2仮想化による割り込みルーティングは関与しません。 割り込みセキュリティ分類 ATFの情報筋から以下のことを確認しました。 すべてのPPIは、汎用GICv3ヘルパーコードによって最初にグループ1非セキュアとして設定されます。 SGI8 (およびオプションで SDEI SGI) のみがセキュアとして再構成されます。 PPI 30 はセキュア割り込みプロパティテーブルに存在しません。 したがって、Generic Timer 割り込みは予想通りグループ1非安全のままのままです。 SCR_EL3.TWE 当初、非セキュアな wfi() が SCR_EL3.TWE を介して EL3 にトラップされるのではないかと疑っていましたが、wfi() が PSCI を介して ATF 自体の中で実行された場合にも同じ動作が発生するため、これは可能性が低いと思われます。 追加調査 ATFのGIC初期化を追跡していると、gicv3_distif_init()がDistributor EnableGrpビットをクリアし、セキュア割り込みプロパティテーブルで要求されたビットのみを再有効化していることに気付きました。 ヘルパーは Group0 と Group1 の Secure プロパティのみを生成するため、EnableGrp1NS が明示的に再度有効になることはないようです。 これを検証するために、我々は以下のことを行いました。 GICD_CTLR を読み込む EnableGrp1NS = 0 を観測しました EL2からEnableGrp1NSを独自に設定しようと試みました。 意外なことに: 書き込みは問題なく完了します。 RWPは正常に動作します。 しかし、読み戻し後もEnableGrp1NSは0のままです。 また、以下の点も確認しました。 GICD_CTLR.DS == 0 GICメモリ領域に対するRDC保護は無効になっています(ENA = 0)。 RDC違反記録はゼロのままです。 したがって、RDCは書き込みを妨げていないようです。 残りの疑問 現時点で、以下の項目を除外しました。 タイマープログラミング、 CPUインターフェース構成、 割り込み優先度マスキング、 割り込みグループ分類、 SCR_EL3.TWE トラッピング、 PSCIと生のWFI実行の比較、 RDC保護。 残された説明のつかない挙動は、アーキテクチャ的に非安全な書き込み可能なディストリビュータ制御ビット(EnableGrp1NS)がこのプラットフォーム上で書き込みを受け入れていないようで、その結果、生のwfi()もPSCIもGeneric Timer割り込みで起動CPU_SUSPENDしないことです。 この動作はi.MX8M Plus Android 15 BSPで予想されるのでしょうか? 汎用タイマーPPIがwfi()からCPUを起動させるために、公開ATFソース以外でプラットフォーム固有の初期化が欠けているのでしょうか? EnableGrp1NSは、このプラットフォーム上で安全でないソフトウェアによる変更を意図的に防いでいるのでしょうか? U-Bootから定期的にウェイクアップする機能を、以下のいずれかの方法で実装することに成功した人はいますか? 生のwfi()、または PSCI CPU_SUSPEND ARMのジェネリックタイマーで動かされているのか? 初期化シーケンスやプラットフォーム固有の動作についてのご意見をいただけると大変ありがたいです。 よろしくお願いします。 よろしくお願いいたします。 桟橋
View full article
ls1021a eTSEC 送信タイムアウト 私はLS1021A IoTと、このCPUをベースにしたプロトタイプ基板を持っています。どちらの場合も、弊社独自のブートローダーを使用しています。 IOTボードでは完璧に動作しますが、私のボードではイーサネットポートで送信タイムアウトが発生します。数回のpingが送信され、その後送信タイムアウトが発生し、さらにpingが送信されます。このため、TFTPはほとんど利用できません。 もちろん、ハードウェアの違いはあります。私たちのMACはBCM54616Sに接続され、その後LAN9514に接続されています。自動交渉の上限は100FDです。ループバックモードでもTXタイムアウトが発生します。 データを送信するためには、ボードのTBI PHYでビットSGMII_ANビットを設定しなければなりませんでしたが、IOTでは不要でした(IOTは1000FDで交渉可能です)。 なぜTXがこんなに断続的に起こるのか分かりません。この速度制限と関係があるのでしょうか? Re: ls1021a eTSEC tx timeout こんにちは、 100FD SGMIIの場合、プロトタイプ基板上のブートローダーで以下の項目を確認してください。 LS1021AのeTSECをSGMII 100Mbpsに設定する ECNTRL[TBIM] = 1 ECNTRL[SGMIIM] = 1 ECNTRL[R100M] = 1 MACCFG2[I/F Mode] = 01 (10/100モードの場合) LS1021Aのリファレンスマニュアルには、SGMII 100Mbpsの場合、 R100M = 1 設定することが明記されています。 内部のTBI PHYをリセットしプログラムするRMは、SGMIIがTBIレジスタセットを使用していること、そしてSGMIIを含むすべてのインターフェースモードでTBIをリセットすることが重要であると述べています。 SGMII_AN ビットは設定したままにしてください。TBI の SGMII_AN ビットは「1 に設定する必要があります」と記載されています。このビットを設定した後にしか基板が送信しないのは驚くことではありません。このPHY/MACモードのブートローダー初期化が不完全であることを示唆しています。 100 Mbps での 1G スタイルの SGMII AN 動作に頼らないでください。LS1021A では、100 Mbps SGMII 動作時に「SGMII リンクが正常ではありません」というメッセージが表示されたり、リンクのサイクル後に断続的にパケットが送信されないという報告が知られていますが、1G 動作では問題ありません。それは、あなたのTXタイムアウトの正確な根本原因を証明するものではありませんが、100FD SGMIIの設定が有力な容疑者であることを示唆しています。 ループバックの結果が重要です。もし「ループバックモード」が外部PHYループバックやSGMII側ループバックであれば、100FDのSGMII/TBIセットアップは関与可能です。内部MAC/eTSECループバックの場合、外部BCM54616S/LAN9514パスはほとんど関係ないので、eTSECの初期化、ディスクリプタリングの処理、キャッシュの一貫性、およびTXの停止/エラー状態に焦点を当てます。 デバッグを行うには、タイムアウトが発生したときにeTSEC TXの停止状態を確認してください。RMは、eTSECがTxBDリングからの送信フレームを処理しなくなったときに送信停止ビットを設定すると述べています。繰り返し可能な原因には、バスエラー、無効なBD/データアドレス、修正不能なBD/データ読み取りエラー、長さ 0 の Ready = 1 などのTxBDプログラミングエラーなどがあります。また、見ているかどうかも確認してください IEVENT_BSY ;NXPの資料では、BSYはバッファ不足やソフトウェアがBDリングに十分速く対応できないことによるRXフレームのドロップと説明されており、これは純粋なSGMIIの電気的症状ではなくソフトウェア/BDリングの症状です。 推奨される分離シーケンス: 1. 必要に 応じて、 外部 PHY を 100FD に 強制し 、 銅線に対する自動ネゴシエーションを無効にします 。2. LS1021Aの MAC / eTSEC を SGMII 100Mbps に 強制的に設定する : TBIM = 1 、 SGMIIM = 1 、 R100M = 1 、 MACCFG2 I / F モード = 10 / 100。3. SGMII モードを設定した後、 TBIを リセット / 再初期化します 。4. TBI SGMII_AN = 1 に設定します 。 5. TBI リンク / AN ステータス 、 eTSEC ECNTRL / MACCFG2 、 および PHY SGMII 側 ステータス を確認します 。6.タイムアウト時に、 IEVENT 、 TXハルトレジスタ、 DMAステータス、およびTXBDリングの内容をダンプします。 敬具 Re: ls1021a eTSEC tx timeout 言い忘れていましたが、私のポートはSGMIIモードに設定されています。 Re: ls1021a eTSEC tx timeout こんにちは、 詳細な調査結果をありがとうございます。ご指摘いただいた回避策(1ミリ秒の遅延、手動によるDMAフラッシュ、 dma-coherent 削除)の組み合わせは、キャッシュエイリアスの問題の典型的なパターンです。以下に、根本原因の説明と推奨される解決方法を示します。 根本原因:TX記述子領域上のキャッシュされた仮想エイリアス LS1021A ENET DMAはキャッシュ整合性のないバス・マスタであり、CPUキャッシュの可視性を持たずにDDRを直接読み込みます。LS1021A上のgianfarの正しい運用モデルは、非コヒーレントなソフトウェア管理モデルです。すなわち、ディスクリプタをキャッシュされていないメモリに割り当て、CPUがディスクリプタフィールドを更新するたびに明示的な dma_sync_* 呼び出しを行います。 LPAEの変更によって最も可能性が高いのは、記述子の物理アドレス範囲のページテーブルエントリに、誤ったキャッシュ属性(デバイスまたは通常のキャッシュ不可ではなく、通常のライトバック)が付与されたことです。これにより、同じ物理メモリに対して異なるキャッシュ性を持つ2つの仮想エイリアスが作成されます。割り当てパス( dma_alloc_noncoherent 経由)はキャッシュされていない状態をマッピングしますが、send関数のパケットごとのTXディスクリプタ更新パスはキャッシュされたエイリアス経由でアクセスします。CPUは更新されたディスクリプタフィールドをキャッシュラインに書き込みますが、それらはDDRに到達せず、ENET DMAは古いデータを読み取ってアンダーランを起こします。 なぜあなたの3つの回避策はすべて同じ欠陥を隠蔽しているのか 1 ms遅延/メッセージ挿入:低負荷時にCPU書き込みバッファが自然に消耗する十分なレイテンシを追加します。タイミング依存で、トラフィックや周波数の変化により故障します。 send 関数で dma_flush 手動で指定すると、DMA がディスクリプタを読み取る前に、PoC へのキャッシュのクリーンアップが強制されます。これは正しい動作ですが、領域が実際にキャッシュされていない場合は不要です。 enet デバイス ノードから dma-coherent 削除すると、カーネルは送信前に各 TX ディスクリプタに対して dma_map_single() / dma_sync_single_for_device() を呼び出し、明示的にキャッシュをクリアします。これも正しく、LS1021A-IOT が送信パスのフラッシュなしで確実に動作した理由を説明しています。 送信パスのフラッシュがないことが、欠けている要素です。LS1021A-IOTは dma-coherent 削除しても動作しました。これは、カーネルのDMAマッピングレイヤーが同期を自動的に挿入したためです。一方、プロトタイプにはそのパスがありません。LPAEの変更により、同期を再導入することなく記述子領域のキャッシュ属性が変更されたためです。 DDR3LとDDR4/周波数の違い これは根本原因ではありません。異なるDRAMの種類や周波数が書き込みレイテンシやバッファのドレインタイミングを変えるため、プロトタイプでは故障がより目立つのですが、根本的な欠陥はアーキテクチャ的なもので、十分な負荷がかかると両方の基板に存在します。 推奨される修正方法 正しく、かつ矛盾のない解決策は、以下の2つを組み合わせることです。 enetデバイスノードから dma-coherent 離しておきましょう(非コヒーレントモデル)。これにより、カーネルDMAレイヤーは、 dma_alloc_noncoherent を介して割り当てられたディスクリプタのDMA所有権が転送される前に、 dma_sync_single_for_device() 自動的に発行します。 TX 送信パスにおいて、各パケットに TX 記述子フィールド ( status 、 data_length 、 data_pointer ) が書き込まれる箇所に、明示的な dma_sync_single_for_device() 呼び出しを追加します。これは手動で追加したフラッシュですが、 TDAR を書く前に正式には dma_sync_single_for_device(dev, desc_dma_addr, sizeof(txbd), DMA_TO_DEVICE) として配置する必要があります。これにより、MMUがディスクリプタ領域をどのように属性付けしても、モデルは明示的かつ正確になります。 別途、ENET記述子に使用される物理アドレス範囲に割り当てられた AttrIndx / TEX+C+B フィールドについて、LPAE MMUライブラリの変更を監査します。ディスクリプタプールは、Device-nGnRnE(厳密な順序付け)またはNormal Non-cacheableとしてマッピングする必要があります。Normal Writebackは使用しないでください。カーネルの ptdump デバッグインターフェースで、割り当て後にディスクリプタプールの仮想アドレスを確認することで、実際に使われている属性を検証できます。 あなたが追加したDMAフラッシュは回避策ではなく、正しい仕組みです。本当の欠陥は、そもそも送信パスにそれが存在していなかったことであり、LPAEの変更によってその領域の実効的なキャッシュ可能性が変わったため、この欠陥が露呈した。   よろしくお願いします。 Re: ls1021a eTSEC tx timeout 送信機能にメッセージを追加したり、1ミリ秒の遅延を設けたりすることで、データの損失なく正しく転送することが可能になります。 送信関数内のTXディスクリプタにDMAフラッシュを追加したところ、改善されました。ただし、ディスクリプタはキャッシュされていないメモリに割り当てられるため、これは必要ないはずです。LPAEサポートを追加したMMUライブラリの欠陥かもしれません。 そういえば、ずいぶん前にenetデバイスノードのdma-coherentプロパティを削除したところ、LS1021A-IOTが動作するようになったことを思い出しました。これは、ディスクリプタ用にキャッシュされていないメモリを割り当てながら、DMAフラッシュを強制的に実行します。しかし、送信関数には、各パケットのTX記述子を更新するキャッシュフラッシュ機能がありませんでした。なぜ私のプロトタイプでは動作しないのか分かりません(周波数の違い、DDR3LとDDR4の違い,...)
View full article
PN7221 fails to detect ISO 14443-3B We ported PN7221 in accordance with the document AN14880 PN7160/PN7220 - Android 16 porting guide. During testing, ISO 14443-3B (NfcB) cards cannot be detected. Moreover, after tapping such a card, the NFC function malfunctions and fails to recognize any cards. It is necessary to toggle NFC off and on again to restore normal operation. Relevant logs are attached below for your analysis. ❯ 07-16 09:24:28.515 530 6384 D NxpTml : PN72xx - I2C Read successful..... 07-16 09:24:28.515 530 6384 D NxpNciR : len = 26 > 61051701010001FF010C0B00000000D103860500808001000000 07-16 09:24:28.515 530 6384 D NxpTml : PN72xx - Posting read message..... 07-16 09:24:28.516 530 6387 D NxpHal : read successful status = 0x0 07-16 09:24:28.516 530 6387 D NxpHal : NxpNci: RF Interface = Frame RF 07-16 09:24:28.516 530 6387 D NxpHal : NxpNci: Protocol = Unknown 07-16 09:24:28.516 530 6387 D NxpHal : NxpNci: Mode = B Passive Poll 07-16 09:24:28.516 530 6387 D NxpHal : NCI NTF: RF_DEACTIVATED len=26 type=1 07-16 09:24:28.517 530 6384 D NxpTml : PN72xx - Read requested..... 07-16 09:24:28.517 530 6384 D NxpTml : PN72xx - Invoking I2C Read..... 07-16 09:24:28.517 1599 6381 D libnfc_nci: rw_t4t_send_to_lower: conn_id sent to lower =0 07-16 09:24:28.517 530 542 I android.hardware.nfc2-service.nxp: write 07-16 09:24:28.517 530 6385 D NxpTml : PN72xx - Write requested..... 07-16 09:24:28.517 530 6385 D NxpTml : PN72xx - Invoking I2C Write..... 07-16 09:24:28.519 530 6385 D NxpNciX : len = 12 > 0000091D0000000000080100 07-16 09:24:28.519 530 6385 D NxpTml : PN72xx - I2C Write successful..... 07-16 09:24:28.519 530 6385 D NxpTml : PN72xx - Posting Fresh Write message..... 07-16 09:24:28.519 530 6385 D NxpTml : PN72xx - Tml Writer Thread Running................ 07-16 09:24:28.519 530 6387 D NxpHal : write successful status = 0x0 07-16 09:24:28.520 530 6384 D NxpTml : PN72xx - I2C Read successful..... 07-16 09:24:28.520 530 6384 D NxpNciR : len = 6 > 600603010001 07-16 09:24:28.520 530 6384 D NxpTml : PN72xx - Posting read message..... 07-16 09:24:28.521 530 6387 D NxpHal : read successful status = 0x0 07-16 09:24:28.521 530 6387 D NxpHal : NCI NTF: CORE_GENERIC_ERROR len=6 07-16 09:24:28.521 530 6384 D NxpTml : PN72xx - Read requested..... 07-16 09:24:28.521 530 6384 D NxpTml : PN72xx - Invoking I2C Read..... 07-16 09:24:28.523 530 6384 D NxpTml : PN72xx - I2C Read successful..... 07-16 09:24:28.523 530 6384 D NxpNciR : len = 5 > 0000020000 07-16 09:24:28.523 530 6384 D NxpTml : PN72xx - Posting read message..... 07-16 09:24:28.523 530 6387 D NxpHal : read successful status = 0x0 07-16 09:24:28.524 1599 6381 I libnfc_nci: rw_t3Bt_sm_get_id (): sub_state:WAIT_ENDEF_FILE_CTRL_TLV (17) 07-16 09:24:28.524 1599 6381 D libnfc_nci: rw_t4t_send_to_lower: conn_id sent to lower =0 07-16 09:24:28.524 530 542 I android.hardware.nfc2-service.nxp: write 07-16 09:24:28.524 530 6385 D NxpTml : PN72xx - Write requested..... 07-16 09:24:28.524 530 6385 D NxpTml : PN72xx - Invoking I2C Write..... 07-16 09:24:28.524 530 6384 D NxpTml : PN72xx - Read requested..... 07-16 09:24:28.524 530 6384 D NxpTml : PN72xx - Invoking I2C Read..... 07-16 09:24:28.525 530 6385 D NxpNciX : len = 8 > 0000050036000008 07-16 09:24:28.525 530 6385 D NxpTml : PN72xx - I2C Write successful..... 07-16 09:24:28.525 530 6385 D NxpTml : PN72xx - Posting Fresh Write message..... 07-16 09:24:28.525 530 6385 D NxpTml : PN72xx - Tml Writer Thread Running................ 07-16 09:24:28.525 530 6387 D NxpHal : write successful status = 0x0 07-16 09:24:28.527 530 6384 D NxpTml : PN72xx - I2C Read successful..... 07-16 09:24:28.527 530 6384 D NxpNciR : len = 6 > 600603010001 07-16 09:24:28.528 530 6384 D NxpTml : PN72xx - Posting read message..... 07-16 09:24:28.528 530 6387 D NxpHal : read successful status = 0x0 07-16 09:24:28.528 530 6387 D NxpHal : NCI NTF: CORE_GENERIC_ERROR len=6 07-16 09:24:28.530 530 6384 D NxpTml : PN72xx - Read requested..... 07-16 09:24:28.530 530 6384 D NxpTml : PN72xx - Invoking I2C Read..... 07-16 09:24:28.531 530 6384 D NxpTml : PN72xx - I2C Read successful..... 07-16 09:24:28.532 530 6384 D NxpNciR : len = 14 > 00000B21CBA4729CB97166900000 07-16 09:24:28.532 530 6384 D NxpTml : PN72xx - Posting read message..... 07-16 09:24:28.532 530 6387 D NxpHal : read successful status = 0x0 07-16 09:24:28.533 1599 6381 I libnfc_nci: rw_t3Bt_sm_get_id (): sub_state:???? UNKNOWN SUBSTATE (18) 07-16 09:24:28.533 1599 6381 I libnfc_nci: nfa_rw_update_pupi_id: 07-16 09:24:28.534 530 6384 D NxpTml : PN72xx - Read requested..... 07-16 09:24:28.534 530 6384 D NxpTml : PN72xx - Invoking I2C Read..... Re: PN7221 fails to detect ISO 14443-3B We've upgraded to version 3.2.5, but the test results remain unchanged. 07-17 01:13:52.157 533 542 D NxpHal : FW version found on the device = 0x30205 Re: PN7221 fails to detect ISO 14443-3B Hello @zhangkai  Please update to 3.2.5, you can get the FW file by going: nfc-NXPNFCC_FW/InfraFW/pn7220 at master · NXP/nfc-NXPNFCC_FW Re: PN7221 fails to detect ISO 14443-3B 06-24 10:20:33.259 390 401 D NxpHal : FW version found on the device = 0x302c4 Re: PN7221 fails to detect ISO 14443-3B Hello @zhangkai  which is the version of FW? if it low 3.2.5, please update to the newest, and test again. If still has question, please provide full log to us. Re: PN7221 fails to detect ISO 14443-3B Hello @zhangkai  Could you provide libnfc-nci.conf and libnfc-nxp.conf files? Re: PN7221 fails to detect ISO 14443-3B Hello @zhangkai This issue may be related to the changes in A16. Specifically: Prior to A15, NXP's mobile MWs relied on NFA_PROTOCOL_T3BT(80) to support ID cards, but A16 has directly included Chinese ID cards in its support scope through Google. However, the PN7xxx MWs still retain this code. Therefore, customers are trying to completely remove the T3BT logic from the PN7xxx MWs and directly use Google's native logic. KaiLi_0-1784790560099.png Re: PN7221 fails to detect ISO 14443-3B The configuration file has been uploaded.
View full article
flex-installer「lsdk2606」バージョンを使用している「imx95-15x15-frdm」Debianで「Weston.Service」に問題が発生しました。 こんにちは、 flex-installerバージョン「 lsdk2606 」を使用してDebianイメージをインストールしました。 ネタバレ (ハイライトして読む) Sudo Flex-installer -I auto -d /dev/sdX -m imx95-15x15-frdm Sudo Flex-installer -I auto -d /dev/sdX -m imx95-15x15-frdm 私のimx95-15x15-frdmでは その後、標準の手順に従ってインストールを続行しました。 ネタバレ (ハイライトして読む) debian-post-install-pkg debian-post-install-pkg すべてのパッケージをインストールし再起動した後、起動時に以下のエラーが発生しました: ネタバレ (ハイライトして読む) [失敗] weston.service - W…nd コンポジターをシステムサービスとして起動できませんでした。 [失敗] weston.service - W…nd コンポジターをシステムサービスとして起動できませんでした。 ネタバレ (ハイライトして読む) root@imx95-15x15-frdm:~# systemctl status weston.service × weston.service - システムサービスとしてのWaylandコンポジタであるWeston ロード済み: ロード済み (/usr/lib/systemd/system/weston.service;有効; プリセット: 有効) アクティブ: 失敗 (結果: 終了コード) 2026年7月20日(月) 13:51:20 UTC以降; 19秒前 呼び出し: 67b22b0fa1484ce681d8b2acdc107add トリガー: ● weston.socket ドキュメント: man:weston(1) man:weston.ini(5) http://wayland.freedesktop.org/ プロセス: 408 ExecStart=/usr/bin/weston --log=${XDG_RUNTIME_DIR}/weston.log --modules=systemd-notify.so (code=exited, status=1/FAILURE) メインPID: 408 (コード=終了、ステータス=1/失敗) メモリピーク:3.5M CPU: 49ms 7月20日 13:51:19 imx95-15x15-frdm systemd[1]: weston.service - WaylandコンポジタであるWestonをシステムサービスとして開始します... 7月20日 13:51:19 imx95-15x15-frdm (weston)[408]: pam_unix(weston-autologin:session): user root(uid=0) by (uid=0) がセッションを開きました 7月20日 13:51:20 imx95-15x15-frdm systemd[1]: weston.service:メインプロセスが終了しました。終了コード=exited、ステータス=1/FAILURE 7月20日 13:51:20 imx95-15x15-frdm systemd[1]: weston.service:結果「exit-code」で失敗しました。 7月20日 13:51:20 imx95-15x15-frdm systemd[1]: weston.service - WaylandコンポジタであるWestonをシステムサービスとして起動できませんでした。 root@imx95-15x15-frdm:~# systemctl status weston.service×weston.service - Wayland コンポジタである Weston をシステム サービスとしてロードしました: ロード済み (/usr/lib/systemd/system/weston.service;有効; プリセット: 有効) アクティブ: 失敗 (結果: 終了コード) 2026年7月20日(月) 13:51:20 UTC以降; 19秒前 呼び出し: 67b22b0fa1484ce681d8b2acdc107add トリガー: ● weston.socketドキュメント: man:weston(1) man:weston.ini(5) http://wayland.freedesktop.org/プロセス:408 ExecStart=/usr/bin/weston --log=${XDG_RUNTIME_DIR}/weston.log --modules=systemd-notify.so (code=exited, status=1/FAILURE) メインPID: 408 (code=exited, status=1/FAILURE) メモリピーク:3.5M CPU: 49ms 7月20日 13:51:19 imx95-15x15-frdm systemd[1]: weston.service - Weston、Waylandコンポジター、システムサービスとして...7月20日 13:51:19 imx95-15x15-frdm (weston)[408]: pam_unix(weston-autologin:session): ユーザーroot(uid=0) by (uid=0) がユーザーroot(uid=0)のためにセッションを開きました by (uid=0) 7月20日 13:51:20 imx95-15x15-frdm systemd[1]: weston.service:メインプロセスが終了しました。コード=exited、ステータス=1/FAILURE 7月20日 13:51:20 imx95-15x15-frdm systemd[1]: weston.service:結果「exit-code」で失敗しました。Jul 20 13:51:20 imx95-15x15-frdm systemd[1]: weston.service - Wayland コンポジタである Weston をシステム サービスとして起動できませんでした。 ネタバレ (ハイライトして読む) root@imx95-15x15-frdm:~# cat /run/user/0/weston.log 日付: 2026年7月20日 UTC [12:34:22.150]ウェストン 14.0.2 https://wayland.freedesktop.org バグ報告先: https://gitlab.freedesktop.org/wayland/weston/issues/ ビルド: LSDK-25.12_DEBIAN-13_LF-6.12.20-168-g2ddc741+ [12:34:22.153]コマンドライン: /usr/bin/weston --log=/run/user/0/weston.log --modules=systemd-notify.so [12:34:22.153]OS: Linux、6.12.49、#5 SMP PREEMPT 2026年5月28日木曜日 13:07:26 KST、aarch64 [12:34:22.153]フライトレコーダー:有効 [12:34:22.155]設定ファイル「/etc/xdg/weston/weston.ini」を使用します。 [12:34:22.156]出力再描画ウィンドウの最大時間は16ミリ秒です。 [12:34:22.158]モジュールの読み込み '/usr/lib/libweston-14/drm-backend.so' [12:34:22.162]モジュールの読み込みに失敗:libdisplay-info.so.1:共有オブジェクトファイルを開けません:そのようなファイルやディレクトリはありません [12:34:22.162]致命的エラー: コンポジターバックエンドの作成に失敗しました root@imx95-15x15-frdm:~# cat /run/user/0/weston.logDate:2026年7月20日 UTC[12:34:22.150]weston 14.0.2https://wayland.freedesktop.orgバグは https://gitlab.freedesktop.org/wayland/weston/issues/Build に報告します。LSDK-25.12_DEBIAN-13_LF-6.12.20-168-g2ddc741+[12:34:22.153]コマンドライン: /usr/bin/weston --log=/run/user/0/weston.log --modules=systemd-notify.so[12:34:22.153]OS: Linux, 6.12.49, #5 SMP PREEMPT 2026年5月28日(木) 13:07:26 KST, aarch64[12:34:22.153]フライトレコーダー:有効[12:34:22.155]設定ファイル「/etc/xdg/weston/weston.ini」を使用しています[12:34:22.156]出力再描画ウィンドウの最大時間は16ミリ秒です。[12:34:22.158]モジュールの読み込み '/usr/lib/libweston-14/drm-backend.so'[12:34:22.162]モジュールの読み込みに失敗しました: libdisplay-info.so.1: 共有オブジェクトファイルを開けません: そのようなファイルやディレクトリはありません[12:34:22.162]致命的エラー: コンポジターバックエンドの作成に失敗しました 私も同じエラーが出ています(関連があるかどうかはわかりませんが)、でも画面には何も表示されません。 ネタバレ (ハイライトして読む) it6263 3-004c: DDC FIFOのクリアに失敗しました it6263 3-004c: EDIDの読み取りに失敗しました it6263 3-004c: DDC FIFOのクリアに失敗しました。it6263 3-004c: EDIDの読み取りに失敗しました。 Re: Issue "Weston.Service" on the "imx95-15x15-frdm" Debian using flex-installe root@imx95-15x15-frdm:~# ldd /usr/lib/libweston-14/drm-backend.so Linux-vdso.so.1 (0x0000ffffac56c000) libweston-14.so.0 => /USR/lib/libweston-14.so.0 (0x0000ffffac410000) libwayland-client.so.0 => /lib/aarch64-Linux-gnu/libwayland-client.so.0 (0x0000ffffac3e0000) libpixman-1.so.0 => /lib/aarch64-linux-gnu/libpixman-1.so.0 (0x0000ffffac330000) libwayland-server.so.0 => /lib/aarch64-linux-gnu/libwayland-server.so.0 (0x0000ffffac2f0000) libdrm.so.2 => /usr/lib/libdrm.so.2 (0x0000ffffac2b0000) libudev.so.1 => /lib/aarch64-linux-gnu/libudev.so.1 (0x0000ffffac250000) libdisplay-info.so.1 => 見つかりません libgbm.so.1 => /usr/lib/libgbm.so.1 (0x0000ffffac220000) libseat.so.1 => /lib/aarch64-linux-gnu/libseat.so.1 (0x0000ffffac1f0000) libinput.so.10 => /lib/aarch64-linux-gnu/libinput.so.10 (0x0000ffffac170000) libc.so.6 => /lib/aarch64-linux-gnu/libc.so.6 (0x0000ffffabfb0000) /lib/ld-linux-aarch64.so.1 (0x0000ffffac520000) libxkbcommon.so.0 => /lib/aarch64-linux-gnu/libxkbcommon.so.0 (0x0000ffffabf40000) libffi.so.8 => /lib/aarch64-linux-gnu/libffi.so.8 (0x0000ffffabf10000) libm.so.6 => /lib/aarch64-linux-gnu/libm.so.6 (0x0000ffffabe60000) libcap.so.2 => /lib/aarch64-linux-gnu/libcap.so.2 (0x0000ffffabe30000) libsystemd.so.0 => /lib/aarch64-linux-gnu/libsystemd.so.0 (0x0000ffffabd00000) Libmtdev.so.1 => /lib/aarch64-linux-gnu/libmtdev.so.1 (0x0000ffffabcd0000) libevdev.so.2 => /lib/aarch64-linux-gnu/libevdev.so.2 (0x0000ffffabc90000) libwacom.so.9 => /lib/aarch64-linux-gnu/libwacom.so.9 (0x0000ffffabc60000) libgudev-1.0.so.0 => /lib/aarch64-linux-gnu/libgudev-1.0.so.0 (0x0000ffffabc30000) libgobject-2.0.so.0 => /lib/aarch64-linux-gnu/libgobject-2.0.so.0 (0x0000ffffabba0000) libglib-2.0.so.0 => /lib/aarch64-linux-gnu/libglib-2.0.so.0 (0x0000ffffaba10000) libatomic.so.1 => /lib/aarch64-linux-gnu/libatomic.so.1 (0x0000ffffab9e0000) libpcre2-8.so.0 => /lib/aarch64-linux-gnu/libpcre2-8.so.0 (0x0000ffffab920000) Re: Issue "Weston.Service" on the "imx95-15x15-frdm" Debian using flex-installe 以下のコマンドを実行して出力を共有してもらえますか? find /usr -name "libdisplay-info*" よろしくお願いします。 Re: Issue "Weston.Service" on the "imx95-15x15-frdm" Debian using flex-installe 最新情報のご提供ありがとうございます。 システム上にはlibdisplay-infoが存在するのがわかりますが、Westonのログはlibdisplay-info.so.1を探しており、インストール済みのライブラリはLibdisplay-info.so.2のようです。 以下のコマンドを実行して出力を共有してもらえますか? ldd /usr/lib/libweston-14/drm-backend.so これにより、ライブラリのバージョン不一致やその他の依存関係の欠落がないかを確認するのに役立ちます。 Re: Issue "Weston.Service" on the "imx95-15x15-frdm" Debian using flex-installe Hello root@imx95-15x15-frdm:~# find /usr -name "libdisplay-info*" /usr/lib/aarch64-linux-gnu/libdisplay-info.so.2 /usr/lib/aarch64-linux-gnu/libdisplay-info.so.0.2.0 /usr/share/doc/libdisplay-info2
View full article