2394875_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2394875_en-US

2394875_en-US

imx8mmini sai1 max sample rates

hi

    sai1 connect a codecs support sample rates 768khz/32bit. SAI1-RX0 connect codec_DOUT.

have no data with 768khz/32bit and L/R channels to read.but SAI1-TXFS/SAI1-TXC could output 768khz/49.152Mhz. read L/R channels with 768khz/16bit and 384khz/32bit is ok.kernel version 6.1.36.

thanks.



Re: imx8mmini sai1 max sample rates

about codecs dts as below:

sofia_0571_0-1784080120640.pngsofia_0571_0-1784080120640.png

run arecord cmd with "-f S32_LE -r 384000 -c 2 -d 1 test.wav" or "-f S16_LE -r 786000 -c 2 -d 1 test.wav" is ok. but run with "-f S32_LE -r 768000 -c 2 -d 1 test.wav",test.wav is NULL.




Re: imx8mmini sai1 max sample rates

Hello,

Could you please share your device tree configuration?

Which CODEC are you using?

Best regards.

Re: imx8mmini sai1 max sample rates

Hello,

If you are getting errors related to the sample rate, could be caused by clock source since it is not able to generate the necessary frequency for that sample rate.

Sometimes, is needed to use a dedicated clock source such as an external clock to get an specific sample rate.

Best regards.

Re: imx8mmini sai1 max sample rateswhen read with 768kHz 32bit x 2 channel,SAI1_TXFS/SAI1_TXC output is ok(768khz/49.152Mhz),The codec data output pin (connect to SAI1_RX0)has data output when checked with an oscilloscope.Is it possible that imx8mmini sdma is not worKing?Re: imx8mmini sai1 max sample rates

Hello,

Do you get underflow or overflow errors during testing?

Best regards.

Re: imx8mmini sai1 max sample rates

get kernel print errors during testing as below:
[ 506.336480] [858] wait_for_avail:1936: asoc-simple-card sound-pcmdev: capture write error (DMA or IRQ trouble?)

Re: imx8mmini sai1 max sample rates

Hello,

Please share your dmesg:

dmesg | grep -i -E "xrun|overrun|dma|fifo|sdma|sai"

With that error log the issue could be caused by an overrun, please try to increase period and buffer size, for example:

arecord -D hw:0,0 -f S32_LE -r 768000 -c 2 --buffer-size=65536 --period-size=8192 -d 5 test.wav

Best regards.

Re: imx8mmini sai1 max sample rates

hi JorgeCas:

 thanks for your reply.

the same error when  increase period and buffer size.

------------------------------------

root@mx8mm:/tmp# arecord -v -D hw:0,0 -f S16_LE -r 768000 -c 2 -d 1 test.wav
Recording WAVE 'test.wav' : Signed 16 bit Little Endian, Rate 768000 Hz, Stereo
Hardware PCM card 0 'pcmdev-audio' device 0 subdevice 0
Its setup is:
stream : CAPTURE
access : RW_INTERLEAVED
format : S16_LE
subformat : STD
channels : 2
rate : 768000
exact rate : 768000 (768000/1)
msbits : 16
buffer_size : 131064
period_size : 16383
period_time : 21332
tstamp_mode : NONE
tstamp_type : MONOTONIC
period_step : 1
avail_min : 16383
period_event : 0
start_threshold : 1
stop_threshold : 131064
silence_threshold: 0
silence_size : 0
boundary : 9222809086901354496
appl_ptr : 0
hw_ptr : 0
root@mx8mm:/tmp# ls test.wav -la
-rw-r--r-- 1 root root 3072044 Jul 22 22:09 test.wav
root@mx8mm:/tmp# arecord -D hw:0,0 -f S32_LE -r 768000 -c 2 --buffer-size=65536 --period-size=8192 -d 5 test.wav
Recording WAVE 'test.wav' : Signed 32 bit Little Endian, Rate 768000 Hz, Stereo
arecord: pcm_read:2221: read error: Input/output error
root@mx8mm:/tmp# dmesg | grep -i -E "xrun|overrun|dma|fifo|sdma|sai"
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000b8400000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vdevbuffer@b8400000, compatible id shared-dma-pool
[ 0.000000] DMA [mem 0x0000000040000000-0x00000000bfffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Policy zone: DMA
[ 0.043871] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[ 0.044176] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.044364] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.105243] iommu: DMA domain TLB invalidation policy: strict mode
[ 0.195002] imx-sdma 302c0000.dma-controller: Direct firmware load for imx/sdma/sdma-imx7d.bin failed with error -2
[ 0.195018] imx-sdma 302c0000.dma-controller: Falling back to sysfs fallback for: imx/sdma/sdma-imx7d.bin
[ 0.199761] mxs-dma 33000000.dma-controller: initialized
[ 1.996379] mmc2: SDHCI controller on 30b60000.mmc [30b60000.mmc] using ADMA
[ 2.786360] mmc1: SDHCI controller on 30b50000.mmc [30b50000.mmc] using ADMA
[ 8.812860] imx-sdma 302c0000.dma-controller: firmware found.
[ 8.818748] imx-sdma 30bd0000.dma-controller: firmware found.
[ 8.825901] imx-sdma 30bd0000.dma-controller: loaded firmware 4.6
[ 91.326700] [857] soc_hw_sanity_check:775: 30010000.sai-pcmdevice-codec: ASoC: pcmdevice-codec <-> 30010000.sai info:
[ 91.326722] [857] soc_hw_sanity_check:777: 30010000.sai-pcmdevice-codec: ASoC: rate mask 0x154c0
[ 91.326728] [857] soc_hw_sanity_check:778: 30010000.sai-pcmdevice-codec: ASoC: ch min 2 max 8
[ 91.326734] [857] soc_hw_sanity_check:780: 30010000.sai-pcmdevice-codec: ASoC: rate min 44100 max 768000
[ 91.342776] [857] fsl_sai_set_bclk:460: fsl-sai 30010000.sai: ratio 2 for freq 24576000Hz based on clock 49152000Hz
[ 91.342784] [857] fsl_sai_set_bclk:481: fsl-sai 30010000.sai: best fit: clock id=1, div=2, deviation =0
[ 91.343315] [857] dapm_update_dai_unlocked:2698: fsl-sai 30010000.sai: Update DAI routes for 30010000.sai capture
[ 113.965788] [861] soc_hw_sanity_check:775: 30010000.sai-pcmdevice-codec: ASoC: pcmdevice-codec <-> 30010000.sai info:
[ 113.965809] [861] soc_hw_sanity_check:777: 30010000.sai-pcmdevice-codec: ASoC: rate mask 0x154c0
[ 113.965816] [861] soc_hw_sanity_check:778: 30010000.sai-pcmdevice-codec: ASoC: ch min 2 max 8
[ 113.965822] [861] soc_hw_sanity_check:780: 30010000.sai-pcmdevice-codec: ASoC: rate min 44100 max 768000
[ 113.977610] [861] fsl_sai_set_bclk:460: fsl-sai 30010000.sai: ratio 1 for freq 49152000Hz based on clock 49152000Hz
[ 113.977618] [861] fsl_sai_set_bclk:481: fsl-sai 30010000.sai: best fit: clock id=1, div=1, deviation =0
[ 113.978149] [861] dapm_update_dai_unlocked:2698: fsl-sai 30010000.sai: Update DAI routes for 30010000.sai capture
[ 124.127055] [861] wait_for_avail:1936: asoc-simple-card sound-pcmdev: capture write error (DMA or IRQ trouble?)
root@mx8mm:/tmp# ls test.wav -la
-rw-r--r-- 1 root root 44 Jul 22 22:09 test.wav
root@mx8mm:/tmp#

Tags (1)
No ratings
Version history
Last update:
‎07-25-2026 02:32 AM
Updated by: