2397625_ja-JP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2397625_ja-JP

2397625_ja-JP

i.MX95 EVKベースボード設計に関する疑問

mrnobody_0-1784709346702.png

これはIMX95ボードに12Vの電源入力がどのように取り込まれるかの回路図です。この設計には少し疑問があります...

1. なぜ20Aのヒューズが2本並列に接続されているのか、40Aの定格電流で行われているのか、それは良い方法なのか?

2. Q2が「オン」のとき、Q2のゲートはGNDに接続されますが、Q2を「オフ」にする際はゲートは浮遊状態のままになります。これは信頼できるのでしょうか?ゲートピンはソース電圧までプルアップすべきでしょうか?

Re: Doubt regarding i.MX95 EVK base board design40Aのヒューズを使わないのはなぜですか?サイズ制限のためですか?Re: Doubt regarding i.MX95 EVK base board design

Q1。突入電流が20Aを超えるため、20A定格のヒューズを2枚(小型サイズ1206)で使用し、コスト効率の高い電流定格を提供するのが良い方法です。

Q2.Q2がオフのとき、そのゲートピンは浮かんだままではなく、100Khmsの抵抗(R197)でソースピンと同じ電源レールに引き上げられ、完全にオフにできます。

Re: Doubt regarding i.MX95 EVK base board design

もし40A定格の小型ヒューズを調達できれば、20Aの20Aヒューズをそれに交換できるでしょう。ヒューズ保護が不要な場合は、ヒューズもショートさせることができます。

Tags (1)
No ratings
Version history
Last update:
3 weeks ago
Updated by: