Connects - Training Material

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connects - Training Material

Training Sessions Material



Home

Home is where the heart is..

Automotive

Silicon Valley 2019 - Automotive Presentation Files

Communication Infrastructure

Edge Intelligence

Industrial

Mobile, Wearable & Computing

IoT Smart Home

Hardware & Software Solutions

Silicon Valley 2019 - Industrial & IoT, Mobile, & Communication Infrastructure Presentation Files

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Multimedia Experience

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Secure Connected & Automated Vehicles

Smart Buildings & Consumer Goods

Secure Mobile, Healthcare & Wearables

Smart Machinery & Industrial Automation

Enabling Design, Technologies & Solutions

Smart Networks & Computing

Secure Connected & Automated Vehicles

Secure Connected & Automated Vehicles

Discussions

Sort by:
The session will provide an overview of the AUTOSAR software for NXP Ethernet products. It will describe the software products, starting from the AUTOSAR standard requirements, but also the extensions implemented to leverage the hardware capabilities of our products. It will also point out the advantages of using the AUTOSAR Switch and Transceiver drivers, from integration with NXP or 3rd party microcontrollers to application use-case diversity and leveraging the software ecosystem and quality requirements set by the automotive industry standards.
View full article
Market and application trends in automotive radar, supporting NCAP and autonomous architectures.
View full article
The raison d'etre of edge computing is processing IoT sensor data, and machine learning techniques are increasingly being used for this analysis. Although general-purpose CPU cores can handle ML, specialized accelerators deliver 10x the performance in the same power envelope. Learn how Layerscape compute and acceleration is addressing the needs today - and see what the future holds.
View full article
This presentation will present a simple EM physics and geometry based approach to designing power distribution networks on PCBs. From input power connection to the IC die, the simple rules discussed can be used to reduce power supply noise and improve EMC. New research presented on the impact of discrete components on radiated and conducted emissions, with an emphasis on cost analysis. Results of recent research on various power supply PCB topology will be discussed.
View full article
NXP leads in the ability to integrate the sensing transducers with the algorithmic computations and the wireless communication channels for TPMS solutions. Leading car OEMs, Tier1s and even tire manufacturers have started to consider and use BLE instead of the standard UHF-band RF interface in TPMS applications. Join this training session to learn about the changing dynamics in TPMS wireless connectivity and the relative merits driving these changes. Further learn about NXPs steps to support these changes with the introduction of a BLE enabled TPMS demo.
View full article
Explore how to build secure CAN connections by using data encryption or CMAC, while taking the best performance on S32K144.
View full article
Adoption of Passive Keyless Entry / Go is growing rapidly, and adding such functionality in the car key introduces challenges for battery life and security. As such, a new class of motion sensor has been developed to address these challenges. In this class, the newest NXP motion sensor, FXLS8962AF, which boasts benchmark power consumption, EMC Class III compliance and full AEC-Q100 qualification is introduced. The sensor has been specifically designed for compatibility with NXP’s all-in-one IC for passive entry keys (i.e. TOKEN), and this class will explain how the two devices are being used together to improve battery life and enhance security in the passive entry system implementation.
View full article
ADAS roadmaps, value proposition, current and future plans for tools and reference designs.
View full article
How to build an automotive application using the S32 SDK, integration with design studio, tips & tricks, FreeRTOS, communication stacks; focus on S32K144 and S32K148.
View full article
This session will cover NXP's complete voice and audio solutions for IoT market. This includes solutions for voice calling, AI voice recognition and music playback. NXP brings complete and optimized audio framework on NXP's MCU and MPU products, which provides ready and easy to use voice and audio functions to IoT developers.  In the applications such as AI speakers, home electrical equipment and voice control nodes.
View full article
In this workshop you will learn about UJA1196 capabilities for HS-CAN communications focused on low-power applications, using its great features for supply voltage, wake-up capabilities, etc. All of this in a very small package.
View full article
This class will cover basic operation and the internal mechanisms of DDR devices. The class will also cover available tools to enable and simplify bring-up and validation of a DDR subsystem.
View full article
Introduction on RCI (Remote Control Interface) for our RF products (Lizard, MantraCS, MantraF). System integration and development made easy using the RCI firmware together with the Configuration Development Kit (CDK).
View full article
Learn how smart amplifier technology from NXP helps your small speakers reach their full potential to maximize user experience.
View full article
A guide to using the Vision SDK for S32V. Learn how to leverage S32V design tools to work with APEX and ISP on the S32V family.  
View full article
Safety by Software (SBSW) is a new way of achieving ASIL-D with high-level measures, supported by NXP S32X hardware. The SBSW hardware module together with SBSW firmware enables to check the user application flow, compare results of main and redundant algorithms and detect faulty behavior with high degree of independence. This session makes you familiar with SBSW usage, configuration, tools, etc.
View full article
S32 Design Studio 3.0 S32V234 focus on configuration tools pin wizard, clocks config, with SDK configuration, FreeRTOS configuration and use building and running a project showing debug with S32 debugger on the m4 with code on target. Configuration tools suite formed from pins, clocks, peripherals, DCD, IVT are offering a complete view of the platform with complete access to all the details directly from the tool and possibility to generate, build and debug the applications.
View full article
Overview of S32K, MagniV and other GPIS products.
View full article
The session includes the overview of S32K Automotive MCU product family for general purpose automotive applications, as well as industrial applications which require automotive quality and reliability. It will cover the introduction of S32K solutions – touch sense, motor control, secured car access, CAN-FD communication, etc.
View full article
Time-Sensitive Networking is the next buzz world in the industrial and automotive Ethernet domain. In this session we will dig into the TSN standards to highlight the key features that are most relevant for the automotive domain. We will also discuss the potential use cases that can be implemented with the SJA1105TEL Automotive Ethernet Switch and discuss the Ecosystem enabling the adoption of such switch in an car.
View full article