i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
Some processor’s GPIO settings on the i.MX Pins Tool version 7 may not show allow to select direction and just show an option “Input/Output” as shown. This will be fixed, but the settings can be changed on the local processor data as a workaround. For more information and documentation for the Pins Tool for i.MX please visit its home page on the link below: https://www.nxp.com/design/designs/pins-tool-for-i-mx-application-processors:PINS-TOOL-IMX   First, find where the Pins Tool data package is stored. To do this open the Pins Tool and click Help > About. On the About screen click the Details button. Take also note of the name of the package that needs to be fixed.   Go to the location where the data package is stored and find the processor data. The file that would need to be updated is signal_configuration.xml    Find the GPIO pin data and change the directions from the string ““inOut”to the string “in out”. Then save this file.    Close and reopen the Pins Tool. The direction on the updated package should now show the options Input and Output.  
View full article
The Linux L4.14.98_1.0.0_GA; and SDK2.5 for 8QM/8QXP Post GA, SDK2.5.1 for 7ULP GA3 release are now available. Linux on IMX_SW web page, Overview -> BSP Updates and Releases -> Linux L4.14.98_2.0.0 SDK on https://mcuxpresso.nxp.com Files available: Linux:  # Name Description 1 imx-yocto-L4.14.98_2.0.0_ga.zip L4.14.98_2.0.0 for Linux BSP Documentation. Includes Release Notes, User Guide. 2 L4.14.98_2.0.0_ga_images_MX6QPDLSOLOX.zip i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualPlus, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo, i.MX 6Solox Linux Binary Demo Files 3 L4.14.98_2.0.0_ga_images_MX6SLLEVK.zip i.MX 6SLL EVK Linux Binary Demo Files 4 L4.14.98_2.0.0_ga_images_MX6UL7D.zip i.MX 6UltraLite EVK, 7Dual SABRESD, 6ULL EVK Linux Binary Demo Files 5 L4.14.98_2.0.0_ga_images_MX7DSABRESD.zip i.MX 7Dual SABRESD Linux Binary Demo Files  6 L4.14.98_2.0.0_ga_images_MX7ULPEVK.zip i.MX 7ULP EVK Linux Binary Demo Files  7 L4.14.98_2.0.0_ga_images_MX8MMEVK.zip i.MX 8MMini EVK Linux Binary Demo Files  8 L4.14.98_2.0.0_ga_images_MX8MQEVK.zip i.MX 8MQuad EVK Linux Binary Demo files 9 L4.14.98_2.0.0_ga_images_MX8QMMEK.zip i.MX 8QMax MEK Linux Binary Demo files 10 L4.14.98_2.0.0_ga_images_MX8QXPMEK.zip i.MX 8QXPlus MEK Linux Binary Demo files 11 imx-scfw-porting-kit-1.2.tar.gz System Controller Firmware (SCFW) porting kit of L4.14.98_2.0.0 12 imx-aacpcodec-4.4.5.tar.gz Linux AAC Plus Codec v4.4.5 13 VivanteVTK-v6.2.4.p4.1.7.8.tgz Vivante Tool Kit v6.2.4.p4.1.7.8   SDK: On https://mcuxpresso.nxp.com/, click the Select Development Board, EVK-MCIMX7ULP//MEK-MIMX8QM/MEK-MIMX-8QX to customize the SDK based on your configuration then download the SDK package.  Target board: MX 8 Series MX 8QuadXPlus MEK Board MX 8QuadMax MEK Board MX 8M Quad EVK Board MX 8M Mini EVK Board MX 7 Series MX 7Dual SABRE-SD Board MX 7ULP EVK Board MX 6 Series MX 6QuadPlus SABRE-SD and SABRE-AI Boards MX 6Quad SABRE-SD and SABRE-AI Boards MX 6DualLite SDP SABRE-SD and SABRE-AI Boards MX 6SoloX SABRE-SD and SABRE-AI Boards MX 6UltraLite EVK Board MX 6ULL EVK Board MX 6ULZ EVK Board MX 6SLL EVK Board What’s New/Features: Please consult the Release Notes.   Known issues For known issues and more details please consult the Release Notes.   More information on changes of Yocto, see: README: https://source.codeaurora.org/external/imx/imx-manifest/tree/README?h=imx-linux-sumo ChangeLog: https://source.codeaurora.org/external/imx/imx-manifest/tree/ChangeLog?h=imx-linux-sumo#
View full article
This documents describes how to add the NFC support to i.MX8M mini evk running Android Pie. Hardware setup: The i.MX8M mini evk (see i.MX 8M Mini Evaluation Kit | NXP) featuring Raspberry Pi compliant connector, the OM5578/RPI PN7150 demo kit can be used to perform this porting (see NFC Development Kits for Arduino and more|NXP). However a small modification must be done because some of the signals required by PN7150 are not mapped to i.MX8M mini expansion connector pins. OM5578 IRQ signal must be mapped to Raspberry Pi connector pin #19 and OM5578 VEN signal must be mapped to Raspberry Pi connector pin #21. See below a picture of the modification: Then, the two boards can fit together as shown in the picture below: Quick start using demo image: The demo image including support for PN7150, is based on Android P9.0.0 Pie (P9.0.0_1.0.0, 4.14 kernel) i.MX software release (see i.MX Software | NXP). Related documentation can be downloaded from here: https://www.nxp.com/docs/en/supporting-information/android_p9.0.0_1.0.0-ga_docs.zip. Just flash the demo image (downloaded from here:https://www.nxp.com/lgfiles/updates/NFC/ANDROID_P9-0-0_PN7150_IMAGE_8MMEVK.zip) following guidelines from i.MX_Android_Quick_Start document (part of Android P9.0.0_1.0.0 Documentation package mentioned above). The NFC support is then included in the device settings, as shown in below screenshot of the device: Approaching the NFC tag, provided as reference in the OM5578 demo kit, to the NFC Antenna will trigger a sound notification: Unfortunately the Android demo image doesn't embed a web browser, so it won't be automatically open when the NFC tag content (an URL to the demo kit web page) is read. Otherwise (if a web browser is installed) you could see such page opening on the device: Adding PN7150 support to imx-android-pie release: If you wish to add PN7150 support to your imx-android-pie environment, just apply the patches (imx-p9.0.0_1.0.0-ga_pn7150_patches.tar.gz file attached) from the ${MY_ANDROID} source code root folder (refer to i.MX_Android_User_Guide document part of Android P9.0.0_1.0.0 Documentation package mentioned above).  $ patch -p1 -d device/fsl/ <device_fsl.patch  $ patch -p1 -d packages/apps/Nfc <packages_apps_Nfc.patch  $ patch -p1 -d hardware/nxp/nfc <hardware_nxp_nfc.patch  $ patch -p1 -d vendor/nxp <vendor_nxp.patch  $ patch -p1 -d vendor/nxp-opensource/kernel_imx/ <vendor_nxp-opensource_kernel_imx.patch When building, the PN7150 support will then be included to the android image, as shown in the demo image described above. Reference: This porting have been done (demo image and patches creation) following guidelines provided in AN11690_NXP-NCI_Android_Porting_Guidelines document.
View full article
The purpose of this document is to provide a guide on how to export new symbols using the Bazel Android server instead of the build_abi.sh script. For a better reference how to build Android i.MX image please look at the next chapter 3 Building the Android Platform for i.MX in the Android User's Guide 1. Compile full AOSP or only kernel Build full AOSP: $ source build/envsetup.sh $ lunch evk_8mp-eng $ ./imx-make.sh -j8  Only build the kernel: $ ./imx-make.sh kernel -j8 2. Generic Kernel Image GKI Development Download GKI outside of android_build (MY_ANDROID). # Make sure MY_ANDROID is set to the android_build folder. $ export MY_ANDROID=`pwd` # mkdir gki && cd gki (Make sure folder gki is not inside of ${MY_ANDROID}) $ repo init -u https://android.googlesource.com/kernel/manifest -b common-android14-6.1 $ repo sync $ cd common 3. Export New Symbols Switch the kernel in this common folder from AOSP to its device, and apply the patches required for your project. In this case Android $ cd common $ git remote add device https://github.com/nxp-imx/linux-imx.git $ git remote update $ git fetch device --tags $ git checkout android-14.0.0_1.2.0 $ cd .. $ ln -s ${MY_ANDROID}/vendor/nxp-opensource/verisilicon_sw_isp_vvcam verisilicon_sw_isp_vvcam $ ln -s ${MY_ANDROID}/vendor/nxp-opensource/nxp-mwifiex nxp-mwifiex $ BUILD_FOR_GKI=yes BUILD_CONFIG=common/build.config.imx $ EXT_MODULES_MAKEFILE="verisilicon_sw_isp_vvcam/vvcam/v4l2/Kbuild" $ EXT_MODULES="nxp-mwifiex/mxm_wifiex/wlan_src" Note: Be sure that your Symbolic Link is pointing to the correct folder Open the Makefile in the following path ../gki/nxp-mwifiex/mxm_wifiex/wlan_src/ and erase some ifreq lines that will generate a No such file or directory error. #Automatically determine Android version from build information to streamline diff --git a/mxm_wifiex/wlan_src/Makefile b/mxm_wifiex/wlan_src/Makefile index 3ec5308..7b6ca47 100644 --- a/mxm_wifiex/wlan_src/Makefile +++ b/mxm_wifiex/wlan_src/Makefile @@ -139,20 +139,7 @@ CONFIG_ANDROID_KERNEL=y ifeq ($(ANDROID_PRODUCT_OUT),1) ccflags-y += -DANDROID_SDK_VERSION=$(ANDROID_SDK_VERSION) else -include $(ANDROID_BUILD_TOP)/build/make/core/build_id.mk -ifeq ($(shell echo "$(BUILD_ID)" | cut -c1),R) - ccflags-y += -DANDROID_SDK_VERSION=30 -else ifeq ($(shell echo "$(BUILD_ID)" | cut -c1),S) - ccflags-y += -DANDROID_SDK_VERSION=31 -else ifeq ($(shell echo "$(BUILD_ID)" | cut -c1),T) - ccflags-y += -DANDROID_SDK_VERSION=33 -else ifeq ($(shell echo "$(BUILD_ID)" | cut -c1),U) - ccflags-y += -DANDROID_SDK_VERSION=34 -else - # Default optimization or actions - ANDROID_SDK_VERSION := 0 - ccflags-y += -DANDROID_SDK_VERSION -endif +ccflags-y += -DANDROID_SDK_VERSION=34 endif endif endif -- Then you could update the symbol list by typing the following command. $ tools/bazel run //common:imx_abi_update_symbol_list After the build process is successful, you should get an output like the image below. Build GKI locally. $ tools/bazel run //common:kernel_aarch64_dist  You could follow the next chapters to update the GKI image to your boot image.
View full article
Information about the transition from the NXP Demo Experience to GoPoint for i.MX Application Processors.
View full article
How to use UART4 on iMX8M from Linux User Space   The UART4 on iMX8MM-EVK and iMX8MN-EVK are thinking of debugging the M core which is not usable on Linux user space by default on pre-compiled images.   To use the UART4 on Linux user space you have to do the next modifications on the device tree and atf to assign that peripheral to Linux User Space     https://github.com/nxp-imx/imx-atf/blob/lf_v2.6/plat/imx/imx8m/imx8mm/imx8mm_bl31_setup.c     iMX8MN-EVK   imx8mn_bl31_setup.c   https://github.com/nxp-imx/imx-atf/blob/lf_v2.6/plat/imx/imx8m/imx8mn/imx8mn_bl31_setup.c   /* Master domain assignment */ RDC_MDAn(RDC_MDA_M7, DID1), /* peripherals domain permission */ - RDC_PDAPn(RDC_PDAP_UART4, D1R | D1W), + RDC_PDAPn(RDC_PDAP_UART4, D0R | D0W), RDC_PDAPn(RDC_PDAP_UART2, D0R | D0W), RDC_PDAPn(RDC_PDAP_RDC, D0R | D0W | D1R),       Device tree configurations for iMX8MN-EVK   iMX8MN-EVK.dtsi   https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx8mn-evk.dtsi   &uart3 { pinctrl-names = "default"; pinctrl-0 = <&pinctrl_uart3>; assigned-clocks = <&clk IMX8MN_CLK_UART3>; assigned-clock-parents = <&clk IMX8MN_SYS_PLL1_80M>; uart-has-rtscts; status = "okay"; }; + &uart4 { + pinctrl-names = "default"; + pinctrl-0 = <&pinctrl_uart4>; + assigned-clocks = <&clk IMX8MN_CLK_UART4>; + assigned-clock-parents = <&clk IMX8MN_SYS_PLL1_80M>; + status = "okay"; + }; ********************** pinctrl_uart3: uart3grp { fsl,pins = < MX8MN_IOMUXC_ECSPI1_SCLK_UART3_DCE_RX 0x140 MX8MN_IOMUXC_ECSPI1_MOSI_UART3_DCE_TX 0x140 MX8MN_IOMUXC_ECSPI1_SS0_UART3_DCE_RTS_B 0x140 MX8MN_IOMUXC_ECSPI1_MISO_UART3_DCE_CTS_B 0x140 >; }; + pinctrl_uart4: uart4grp { + fsl,pins = < + MX8MN_IOMUXC_UART4_RXD_UART4_DCE_RX 0x140 + MX8MN_IOMUXC_UART4_TXD_UART4_DCE_TX 0x140 + >; + };   iMX8MM-EVK   https://github.com/nxp-imx/imx-atf/blob/lf_v2.6/plat/imx/imx8m/imx8mm/imx8mm_bl31_setup.c   imx8mm_bl31_setup.c   /* Master domain assignment */ RDC_MDAn(RDC_MDA_M7, DID1), /* peripherals domain permission */ - RDC_PDAPn(RDC_PDAP_UART4, D1R | D1W), + RDC_PDAPn(RDC_PDAP_UART4, D0R | D0W), RDC_PDAPn(RDC_PDAP_UART2, D0R | D0W), RDC_PDAPn(RDC_PDAP_RDC, D0R | D0W | D1R),   Device tree configurations for iMX8MM-EVK   iMX8MM-EVK.dtsi   https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx8mm-evk.dtsi   &uart3 { pinctrl-names = "default"; pinctrl-0 = <&pinctrl_uart3>; assigned-clocks = <&clk IMX8MM_CLK_UART3>; assigned-clock-parents = <&clk IMX8MM_SYS_PLL1_80M>; uart-has-rtscts; status = "okay"; }; + &uart4 { + pinctrl-names = "default"; + pinctrl-0 = <&pinctrl_uart4>; + assigned-clocks = <&clk IMX8MM_CLK_UART4>; + assigned-clock-parents = <&clk IMX8MM_SYS_PLL1_80M>; + status = "okay"; + }; ********************** pinctrl_uart3: uart3grp { fsl,pins = < MX8MM_IOMUXC_ECSPI1_SCLK_UART3_DCE_RX 0x140 MX8MM_IOMUXC_ECSPI1_MOSI_UART3_DCE_TX 0x140 MX8MM_IOMUXC_ECSPI1_SS0_UART3_DCE_RTS_B 0x140 MX8MM_IOMUXC_ECSPI1_MISO_UART3_DCE_CTS_B 0x140 >; }; + pinctrl_uart4: uart4grp { + fsl,pins = < + MX8MM_IOMUXC_UART4_RXD_UART4_DCE_RX 0x140 + MX8MM_IOMUXC_UART4_TXD_UART4_DCE_TX 0x140 + >; + };   iMX8MP-EVK   https://github.com/nxp-imx/imx-atf/blob/lf_v2.6/plat/imx/imx8m/imx8mp/imx8mp_bl31_setup.c   imx8mp_bl31_setup.c   RDC_MDAn(RDC_MDA_M7, DID1), RDC_MDAn(RDC_MDA_LCDIF, DID2), RDC_MDAn(RDC_MDA_LCDIF2, DID2), RDC_MDAn(RDC_MDA_HDMI_TX, DID2), /* peripherals domain permission */ + RDC_PDAPn(RDC_PDAP_UART4, D0R | D0W), RDC_PDAPn(RDC_PDAP_UART2, D0R | D0W), RDC_PDAPn(RDC_PDAP_WDOG1, D0R | D0W), RDC_PDAPn(RDC_PDAP_RDC, D0R | D0W | D1R),   Device tree configurations for iMX8MP-EVK   iMX8MP-EVK.dts   https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx8mp-evk.dts   &uart3 { pinctrl-names = "default"; pinctrl-0 = <&pinctrl_uart3>; assigned-clocks = <&clk IMX8MP_CLK_UART3>; assigned-clock-parents = <&clk IMX8MP_SYS_PLL1_80M>; fsl,uart-has-rtscts; status = "okay"; }; + &uart4 { + pinctrl-names = "default"; + pinctrl-0 = <&pinctrl_uart4>; + assigned-clocks = <&clk IMX8MP_CLK_UART4>; + assigned-clock-parents = <&clk IMX8MP_SYS_PLL1_80M>; + status = "okay"; + }; ************************************ pinctrl_uart3: uart3grp { fsl,pins = < MX8MP_IOMUXC_ECSPI1_SCLK__UART3_DCE_RX 0x140 MX8MP_IOMUXC_ECSPI1_MOSI__UART3_DCE_TX 0x140 MX8MP_IOMUXC_ECSPI1_SS0__UART3_DCE_RTS 0x140 MX8MP_IOMUXC_ECSPI1_MISO__UART3_DCE_CTS 0x140 >; }; + pinctrl_uart4: uart4grp { + fsl,pins = < + MX8MP_IOMUXC_UART4_RXD__UART4_DCE_RX 0x140 + MX8MP_IOMUXC_UART4_TXD__UART4_DCE_TX 0x140 + >; + };     After compiling the image with the changes previously shown, we obtained this result:      
View full article
Introduction ARM SoC+FPGA/CPLD is widely used in some application like industry control and data acquisition system, there were many customers adopted i.MX6 EIM (a memory parallel interface) to access FPGA/CPLD, and archived good data throughput, but EIM is removed from i.MX8M and i.MX9, some customers is asking for such a compatible solution for i.MX8/8M and coming i.MX9 family.  FlexSPI is designed for connecting storage devices like NOR Flash, integrated in most of i.MXRT/i.MX8/LS products and provides flexible configuration for 4-wire/8wire working mode, this article provides a low-cost and efficiency demo to show how  to support CPLD/FPGA  via FlexSPI, as a replacement of EIM for EP i.MX8/9/LS products. key features Implement a  new kernel driver for FlexSPI to support read/write access to FPGA/CPLD. Support two type connections: Support 4-wire(QSPI) and 8-wire(HypeBUS, OctalSPI) Deliverables A new kernel driver for FlexSPI to support read/write access to FPGA/CPLD by AHB command A kernel patch to disable the QSPI Flash in kernel A test program shows how to do read/write performance test. Hardware Hardware Prepare: i.MX8MM-LPDDR4-EVK Lattice LFE5U EVK Figure1 4-wire SPI HW Block diagram Figure2 8-wire OctalSPI   Hardware Rework on i.MX8MM-EVK     1 Need to remove the SPI-Flash(U5, MT25QU256ABA) on the i.MX8MM-EVK board, and wire below signals: QSPI_DATA0 QSPI_DATA1 QSPI_DATA2 QSPI_DATA3 QSPI_SCLK QSPI_nSS0 VDD_1V8 GND Figure3 QPSI signals for FPGA/CPLD Figure4 Hardware rework on i.MX8MM-EVK board Note that, i.MX8MM-EVK QSPI power rails is 1.8v, so be careful that the FPGA/CPLD side IO should be 1.8V. Software BSP version 1 Linux BSP version: L5.10.52 Software Change  Apply 0001-FlexSPI-FPGA-need-to-disable-flexspi-for-fpga-usage.patch in Linux kernel and generate the new dtb extract the flexspi-fpga driver compile the flexspi-fpga driver with the kernel$ $make -C $(YOUR_KDIR) M=$(FlexSPI_FPGAW_DIVER_DIR) modules ARCH=arm64 CROSS_COMPILE=$(CROSS_COMPILE) Deployment  upload new generated i.mx8mm-evk.dtb to the target board(the 1st partition) upload the flex-spi driver and fpga/cpld test program to the target board   Test Test1: Set the flexspi working at 40Mhz   $insmod imx_flexspi_fpga.ko pre_div=2 post_div=5 Read/write FPGA/CPLD test .$/flexspi_fpga_test -p 0x08000000 -s 768 Test2: Set the FlexSPI working at 100MHz   $ insmod imx_flexspi_fpga.ko pre_div=1 post_div=4 Read/write FPGA/CPLD test $./flexspi_fpga_test -p 0x08000000 -s 768   Limitation FPGA and Flash devices can’t work at the same time due to just one FlexSPI controller. Due to the IO assignment conflict in i.MX8M EVK design, this demo just tested 4-wire(QSPI) mode at 50MHz and got data throughput as expected. Disclaimer: − “Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.”
View full article
Hello everyone, this document will share an step by step guide of the configuration needed in a Linux PC to compile the SDK examples we provide, as well as how to download them in an easy way. Requirements: I.MX 8M Mini EVK SDK package (for i.MX8MM) UUU tool First step would be to get the SDK package, this include documentation and code, which is available at the MCUXpresso builder webpage: https://mcuxpresso.nxp.com/en/welcome Click on the select a development board and select the package for your development kit or the i.MX MPU   This guide is focused on Linux build so will select GCC package and Linux host PC as the environment. Click on build and wait for the SDK package to be ready for download. Note1: Click on select all if the whole middleware package is desired Note2: it is possible to select each middleware that are desired. On new window select download SDK Select on new pop-up window download both SDK and documentation Read and accept EULA so the download start Decompress the package using the following command: $ tar -xvzf ~/SDK_2_13_0_EVK-MIMX8MM.tar.gz -C ~/SDK_2_13_0_EVK-MIMX8MM Next will be to download the GCC from the ARM webpage, gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2 https://developer.arm.com/downloads/-/gnu-rm Note that the GCC version used is based on the minimum version required, since this was tested and supported, this could be found within the SDK documentation (~/SDK_2_13_0_EVK-MIMX8MM/docs/MCUXpresso SDK Release Notes for EVK-MIMX8MM) Once downloaded we can decompress and configure the environment: $ tar -xf gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2 $ export ARMGCC_DIR=~/gcc-arm-none-eabi-10.3-2021.10 $ export PATH=$PATH:~/gcc-arm-none-eabi-10.3-2021.10 $ sudo apt-get install cmake  Check the version >= 3.0.x $ cmake --version Once this is done we enter the path of the example of our choice and compile using the script, as necessary using debug, release or all. $ cd ~/SDK_2_13_0_EVK-MIMX8MM/boards/evkmimx8mm/demo_apps/hello_world/armgcc $./build_release.sh The binary (elf and bin) will be found inside the folder according to whether we use debug or release script. For this example we used release script: $ cd release Once builded we can move/download the binaries from the Linux host PC to the board by using the UUU tool with the command fat_write #### we put the board in fastboot mode by entering the command in the uboot terminal fastboot 0 #### From the Linux terminal introduce the UUU command to  download to the FAT partition of the eMMC of the baord: ## For rproc it is needed the .elf binary ## $ uuu -v -b fat_write hello_world.elf mmc 0:1 hello_world.elf ## For bootaux it is needed the .bin binary ## $  uuu -v -b fat_write hello_world.bin mmc 0:1 hello_world.bin Once with the binaries in the FAT partition of the SD/eMMC of our board we can make the necessary modifications (device tree/bootargs) to test the Cortex-M examples. For any question regarding this document, please create a community thread and tag me if needed. Saludos/Regards, Aldo.
View full article
current bsp fixed the lvds pixel clock up to 74.25Mhz for single channel and 148.5Mhz for dual channel, if customer wants to know why and how to change it, maybe can refer to the enclosed file, hope helpful for you
View full article
In the i.MX 8M Plus LPDDR4 EVK board there are two Type-C port design. For the port0 is used to power supply no usb function, for the port1 used for USB function but without PD function. But in customer’s design, customer only use one USB design on their board, how to make the one USB work with the PD and USB function, we need to make the hardware design and software modify. This article only give method to realized it and have tested and realized the port1 PD function. 1 Introduction of the USB interface on i.MX8MP         There are two USB 3.0 TypeC controllers with integrated PHY interface on the i.MX8MP: Backward compatibility with USB 2.0 Spread spectrum clock support   The USB on the i.MX8MP supports USB3.0 and is compatible with USB2.0 downward. We can see that the upper layer is the universal layer for USB 2.0 and USB 3.0 operations. This is a common interface, buffer management block, list processor, used to schedule and control the status register (CSR) function: USB 2.0 physical layer and MAC layer USB 3.0 physical layer, link layer and MAC layer   Features of USB 3.0: USB compliant version 3.0 (xHCI compatible) Supports operation as a stand-alone USB host controller USB dual role operation, configurable as host or device Ultra high speed (5Gbit/s), high speed (480Mbit/s), full speed (12Mbit/s) and low speed (1.5Mbit/s) operation. Support independent single port USB operation Support for four programmable bidirectional USB endpoints Support system memory interface with 40 bit addressing capability   2 Design of USB on Development Board         The i.MX 8M Plus processor includes two USB 2.0/3.0 controllers and two integrated USB PHYs. USB supports both running as an independent USB host controller and dual role USB operation, and can be configured as a host or device. Therefore, the design of these two functions is implemented on the development board of i.MX8MP.   We can see that on the development board, one USB1 is used for the USB Type-C port and the other USB2 is used for the USB 3.0 host port. USB Type-C port 0 (J5) is only used for power supply. It does not support USB data transfer. It is the only power port, so the system must always be powered.   On the CPU side of the schematic diagram, we can also see that USB1 is the port for USB Type-C, and USB2 is the host for USB3.0.    USB1 is designed as USB Type-C:   USB2 USB3.0 Host design:   Power design of the USB Type-C port:   3 Only one USB interface is used in the design (compatible with both USB PD function and USB dual roles function)         Two USB Type-C ports are used on our development board. One is used to power the board separately, and the other is used as the function of USB Type-C. However, due to the limited design cost and chip layout and space on the board, some customers will use a USB interface to realize the dual role function of power supply and USB. How to achieve this? USB Device(Download mode):     USB Host mode(power+device Need the hub support PD function):     The specific implementation and design are as follows: 3.1 Hardware realize PTN5110 To realize the USB Type-C support power supply function, PTN5110 (USB PD TCPC PHY IC) chip is required to realize Type-C data logic and power control and management. The selection of PTN5110 is critical and important.   PTN5110 is a single port USB PD (power supply) PHY IC that conforms to TCPC. It integrates Type-C configuration channel (CC) interface and USB PD physical layer functions into Type-C port manager (TCPM) that handles PD policy management. It complies with USB PD, Type-C and TCPC specifications.   The IC is mainly aimed at applications in system platforms (such as laptops, desktops, Chromebooks, tablets, flip notebooks, etc.). Other application cases may be feasible, depending on the application architecture, such as docking stations, displays, accessories, cable adapters, smartphones, etc.   It can support various Type-C applications: Sink, Source, Sink with accessory support or DRP. It executes Type-C CC simulation part (i.e. Rd/Rp/Ra detection, Rd/Rp indication) and PD Tx/Rx PHY and protocol state machine. PTN5110 supports TCPM in the system implementation of the following PD roles.   PTN5110 integrates VCONN load switch, programmable current limit, reverse leakage current blocking and over temperature protection (OTP). It is equipped with two enable control outputs to control the load switch/FET in the VBUS pull and/or sink path. It can also perform VBUS voltage monitoring/measurement, VBUS forced discharge and discharge discharge.   PTN5110 provides the main IO related functions for the main processor/TCPM, so that Type-C/PD interfaces can be easily controlled and managed through the TCPC interface.   PTN5110 supports a wide range of power input voltages, providing platform integrators with great flexibility. PTN5110 can run on VBUS to support specific system use cases that require no power operation.https://www.nxp.com/products/interfaces/usb-interfaces/usb-type-c/usb-pd-phy-and-cc-logic/usb-pd-tcpc-phy-ic:PTN5110   The design only use the USB1:   Here, it is required to weld R53 or R54. You can refer to this design completely. 2 Software modify Modify the BPS of the software: Take the newest released Linux 5.15.32_2.0.0​ as example: In the u-boot /board/freescale/imx8mp_evk/imx8mp_evk.c     It can be seen that the PD function of the port is turned off, so if you want to use USB1 for power supply, remove the following commands and turn on the PD function of USB1. “-   .disable_pd = true,” Use the above action to enable Port1 PD function. Kernel section modify: Kernel section modify towards to PTN5110. Type-C Configure channel (CC) interface: root/drivers/usb/typec/tcpm/tcpci.c @@ -524,6 +524,7 @@ static int tcpci_vbus_force_discharge(struct tcpc_dev *tcpc, bool enable)  static int tcpci_set_vbus(struct tcpc_dev *tcpc, bool source, bool sink)  {        struct tcpci *tcpci = tcpc_to_tcpci(tcpc); +      unsigned int reg;        int ret;          if (tcpci->data->set_vbus) { @@ -533,16 +534,20 @@ static int tcpci_set_vbus(struct tcpc_dev *tcpc, bool source, bool sink)                         return ret < 0 ? ret : 0;        }   +      ret = regmap_read(tcpci->regmap, TCPC_POWER_STATUS, &reg); +      if (ret < 0) +              return ret; +        /* Disable both source and sink first before enabling anything */   -       if (!source) { +      if (!source && (reg & TCPC_POWER_STATUS_SOURCING_VBUS)) {                 ret = regmap_write(tcpci->regmap, TCPC_COMMAND,                                     TCPC_CMD_DISABLE_SRC_VBUS);                 if (ret < 0)                         return ret;        }   -       if (!sink) { +      if (!sink && (reg & TCPC_POWER_STATUS_SINKING_VBUS)) {                 ret = regmap_write(tcpci->regmap, TCPC_COMMAND,                                     TCPC_CMD_DISABLE_SINK_VBUS);                 if (ret < 0)   Type-C port manager managed by PD (TCPM): root/drivers/usb/typec/tcpm /tcpm.c @@ -340,6 +340,7 @@ struct tcpm_port {         */        bool vbus_vsafe0v;   +      bool vbus_keep;        bool vbus_never_low;        bool vbus_source;        bool vbus_charge; @@ -3662,7 +3663,8 @@ static void tcpm_reset_port(struct tcpm_port *port)        port->rx_msgid = -1;          port->tcpc->set_pd_rx(port->tcpc, false); -       tcpm_init_vbus(port);     /* also disables charging */ +      if (!port->vbus_keep) +              tcpm_init_vbus(port);  /* also disables charging */        tcpm_init_vconn(port);        tcpm_set_current_limit(port, 0, 0);        tcpm_set_polarity(port, TYPEC_POLARITY_CC1); @@ -5834,6 +5836,9 @@ static void tcpm_init(struct tcpm_port *port)          port->tcpc->init(port->tcpc);   +      port->vbus_present = port->tcpc->get_vbus(port->tcpc); +      if (port->vbus_present) +              port->vbus_keep = true;        tcpm_reset_port(port);          /* @@ -5872,7 +5877,10 @@ static void tcpm_init(struct tcpm_port *port)         * Some adapters need a clean slate at startup, and won't recover         * otherwise. So do not try to be fancy and force a clean disconnect.         */ -       tcpm_set_state(port, PORT_RESET, 0); +      if (!port->vbus_keep) +              tcpm_set_state(port, PORT_RESET, 0); + +      port->vbus_keep = false;  }    static int tcpm_port_type_set(struct typec_port *p, enum typec_port_type type) Note: The software just needs to modify these two parts. You also need to mention to the proper the I2C port use, if not proper the driver of the PTN5110 can not driver. 4 Test         In our i. MX8MP EVK development board show that R53 and R54 in the USB1 part of our development board are in DNP status, so VBUS_ IN is disconnected and no power comes in. Here, connect R53 or R54 with solder, so that VBUS_ IN, the power comes in again. After the power is connected. The board can be powered through USB1. 4.1 Download images to the emmc on the Board: Power from the USB1, set the boot mode to serial download mode, then go to download images finished. 4.2 Boot up the board from the EMMC Change the boot mode to boot up from EMMC,the board boot up, the log file is as following show:   It will stop at the TCPC for the section of PTN5110 driver. By default, the PD function of port1 in the u-boot is turned off, so if you want to use USB1 for power supply, remove the following commands and turn on the PD function of USB1. “-   .disable_pd = true,” After the PD function is turned on, the board can be started normally, but the whole part running to the kernel will be powered down, so the kernel part of PTN5110 still needs to be modified. After the patch modification of the above kernel part, the board can run normally.         I also did the same experiment on the i.MX8MM EVK development board. The same phenomenon occurs when the kernel starts. Therefore, similar modifications to the above i. MX8MP can work normally. Summary: In one word i.MX8MP and i.MX8M series can realize the role of using a USB for power supply and USB Dual. The hardware design refers to our development board, and we must use the logic chip PTN5110. For software, refer to the above code modification.  
View full article
  Anyone who want to use this solution should get reference design and firmware from Lontium. Hardware Here is the block diagram of LT9611UXC Demo Board. As the MIPI port of our EVK can provide 5V, 3V3 and 1V8.We can remove useless DC-DC chips from reference design. Below is the LT9611UXC Demo Board. Software Download the firmware into LT9611UXC. In Linux side, we need to drive the MIPI to output signals with standard timings of 1080P. Panel type diff --git a/arch/arm64/boot/dts/freescale/imx8mp-evk.dts b/arch/arm64/boot/dts/freescale/imx8mp-evk.dts index 1732b5c72380..c6a829be541f 100644 --- a/arch/arm64/boot/dts/freescale/imx8mp-evk.dts +++ b/arch/arm64/boot/dts/freescale/imx8mp-evk.dts @@ -696,13 +716,17 @@ &ldb_phy { &mipi_dsi { status = "okay"; + panel@0{ + compatible = "nxp,lt9611uxc"; + reg = <0>; + status = "okay"; }; }; &snvs_pwrkey { diff --git a/drivers/gpu/drm/panel/panel-simple.c b/drivers/gpu/drm/panel/panel-simple.c index 4f78bbf63f33..90d99f12515b 100644 --- a/drivers/gpu/drm/panel/panel-simple.c +++ b/drivers/gpu/drm/panel/panel-simple.c @@ -4997,6 +4997,34 @@ struct panel_desc_dsi { unsigned int lanes; }; +static const struct drm_display_mode lt9611_panel_mode = { + .clock = 148500, + .hdisplay = 1920, + .hsync_start = 1920 + 88, + .hsync_end = 1920 + 88 + 44, + .htotal = 1920 + 88 + 44 + 148, + .vdisplay = 1080, + .vsync_start = 1080 + 4, + .vsync_end = 1080 + 4 + 5, + .vtotal = 1080 + 4 + 5 + 36, +}; + +static const struct panel_desc_dsi lt9611_panel = { + .desc = { + .modes = &lt9611_panel_mode, + .num_modes = 1, + .bpc = 8, + .size = { + .width = 62, + .height = 110, + }, + .connector_type = DRM_MODE_CONNECTOR_DSI, + }, + .flags = MIPI_DSI_MODE_VIDEO_HSE | MIPI_DSI_MODE_VIDEO | MIPI_DSI_MODE_NO_EOT_PACKET | MIPI_DSI_MODE_VIDEO_SYNC_PULSE, + .format = MIPI_DSI_FMT_RGB888, + .lanes = 4, +}; + static const struct drm_display_mode auo_b080uan01_mode = { .clock = 154500, .hdisplay = 1200, @@ -5201,6 +5229,9 @@ static const struct panel_desc_dsi osd101t2045_53ts = { static const struct of_device_id dsi_of_match[] = { { + .compatible = "nxp,lt9611uxc", + .data = &lt9611_panel, + },{ .compatible = "auo,b080uan01", .data = &auo_b080uan01 }, {
View full article
Purpose This is early communication to notify i.MX 8M Dual/8M QuadLite/8M Quad customers of a potential incorrect PCIe power supply configuration on certain NXP BSP Linux and Android versions. Description The PCIE_VPH power supply is selectable in software  between 1.8V and 3.3V. When the PCIE_VPH supply is configured to operate at 3.3V, the 1.8V internal regulator (disabled by default) must be enabled to prevent overstress conditions on the PCIe PHY. If the 1.8V internal regulator is left disabled when the PCIE_VPH supply is configured to operate at 3.3V, it could potentially impact the product lifetime of the device.   Impact •i.MX 8M Dual/8M QuadLite/8M Quad (other i.MX processors are not impacted) •Only Impacts Linux/Android kernel versions earlier than L5.4.70_2.3.2 or Linux 5.10.9_1.0.0 releases MITIGATION •When the PCIE_VPH supply is configured to operate at 3.3V users need to enable the internal regulator by setting the IOMUXC_GPR_GPR14 and IOMUXC_GPR_GPR16 registers - PCIE1_VREG_BYPASS and PCIE2_VREG_BYPASS bit to 0. •There are 3 software patches for each release. Software patch details in the Code Aurora Forum (CAF): •For L5.4.70_2.3.2 patch release, the git log references are: •MLK-25349-3 PCI: imx: clear vreg bypass when pcie vph voltage is 3v3 •MLK-25349-2 arm64: dts: imx8mq-evk: add one regulator used to power up pcie phy •MLK-25349-1 dt-bindings: imx6q-pcie: add one regulator used to power up pcie phy • •The L5.4.70_2.3.2, LF_5.10 Q2 and later BSP releases correctly configure and enable the internal regulator by setting the IOMUXC_GPR_GPR14 and IOMUXC_GPR_GPR16 registers The Patch MLK-25349 which correctly enables the internal regulator is already included in the L5.4.70_2.3.2 patch release and release versions after it. MITIGATION •The following branches of Linux/Android BSP releases contain the MLK-25349 patch. The patch is attached below for each respective release.   •Other branches which are not listed should try to apply the nearest Patch version patch. If a user encounters any conflicts in applying, they should back porting from below nearest patch release version below. imx_4.9.51_ga, imx_4.9.y_android_imx8m_ga_v2                           - Patch attached  imx_4.9.88_ga, imx_4.9.y_android_2.0.0_ga                                   - Patch attached  imx_4.14.y and imx_4.14.98_2.3.0, imx_4.14.98_2.3.0_android     - Patch attached  imx_4.19.y and imx_4.19.35_1.1.0, imx_4.19.35_1.1.0_android     - Patch attached  imx_5.4.y, imx_5.4.3_2.0.0, imx_5.4.3_2.0.0_android                     - Patch attached Documentation Change Description – 1 of 3 for Datasheet Updated Datasheets and Reference Manual will be published to nxp.com. Updated Hardware Design guide and Schematics have already been published on nxp.com.  Updated the descriptions of PCIE_VPH in the Datasheet Table 8, "Operating ranges"     Documentation Change Description – 2 of 3 for Reference Manual (RM) Updated the description of field 12 "PCIE1_VREG_BYPASS" in 8.2.4.15 GPR14 General Purpose Register (IOMUXC_GPR_GPR14)           Documentation Change Description – 3 of 3 for RM Updated the description of field 12 "PCIE2_VREG_BYPASS" in 8.2.4.17 GPR16 General Purpose Register (IOMUXC_GPR_GPR16)   REFERENCES •i.MX 8M Dual / 8M QuadLite / 8M Quad Product Lifetime Usage  •i.MX 8M Dual / 8M QuadLite / 8M Quad Applications Processors Data Sheet for Industrial Products •i.MX 8M Dual / 8M QuadLite / 8M Quad Applications Processors Data Sheet for Consumer Products •i.MX 8MDQLQ Hardware Developer’s Guide  •i.MX 8M Dual/8M QuadLite/8M Quad Applications Processors Reference Manual  
View full article
   Some of Chinese customer couldn’t normally download android source code from google site, here give a way to download android source from Mirror site of Tsinghua University. Customers in other areas can refer to the configurations of ubuntu 18.04 in the document. Updating software packages for ubuntu18.04 LTS 1、Using software updater to update software packages Press Install Now button to update software. Restart ubuntu18.04 2、Installing necessary software packages #sudo apt-get install flex # sudo apt-get install bison # sudo apt-get install gperf # sudo apt-get install build-essential # sudo apt-get install zlib1g-dev # sudo apt-get install lib32ncurses5-dev # sudo apt-get install x11proto-core-dev # sudo apt-get install libx11-dev # sudo apt-get install lib32z1-dev # sudo apt-get install libgl1-mesa-dev # sudo apt-get install tofrodos # sudo apt-get install python-markdown # sudo apt-get install libxml2-utils # sudo apt-get install xsltproc # sudo apt-get install uuid-dev:i386 liblzo2-dev:i386 # sudo apt-get install gcc-multilib g++-multilib # sudo apt-get install subversion # sudo apt-get install openssh-server openssh-client # sudo apt-get install uuid uuid-dev # sudo apt-get install zlib1g-dev liblz-dev # sudo apt-get install liblzo2-2 liblzo2-dev # sudo apt-get install lzop # sudo apt-get install git-core curl # sudo apt-get install u-boot-tools # sudo apt-get install mtd-utils # sudo apt-get install android-tools-fsutils # sudo apt-get install openjdk-8-jdk # sudo apt-get install device-tree-compiler # sudo apt-get install aptitude # sudo aptitude install libcurl4-openssl-dev nss-updatedb 3、Downloading and unpacking Android release package https://www.nxp.com/products/processors-and-microcontrollers/applications-processors/i.mx-applications-processors/android-os-for-i.mx-applications-processors:IMXANDROID?tab=Design_Tools_Tab --O8.1.0_1.3.0_ANDROID_SOURCE_8MQ_GA File name is imx-o8.1.0_1.3.0_8m.tar.gz # cd ~ # tar xzvf imx-o8.1.0_1.3.0_8m.tar.gz Downloading android8.1.0-1.3.0 source code Getting repo # cd ~ # mkdir bin # cd bin # curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo # chmod a+x ~/bin/repo # export PATH=${PATH}:~/bin   Modifying repo File Open ~/bin/repo file with 'gedit' and Change google address From REPO_URL = 'https://gerrit.googlesource.com/git-repo' To REPO_URL = 'https://mirrors.tuna.tsinghua.edu.cn/git/git-repo/' 3、Setting email address # git config --global user.email "xxxx@nxp.com" # git config --global user.name "xxxx" [ Email & Name should be yours] 4、Modifying android setup script and Running it Open ~/ imx-o8.1.0_1.3.0_8m /imx_android_setup.sh and add a line like below: ...       if [ "$rc" != 0 ]; then          echo "---------------------------------------------------"          echo "-----Repo Init failure"          echo "---------------------------------------------------"          return 1       fi find -name 'aosp-O8.1.0-1.3.0.xml'| xargs perl -pi -e 's|https://android.googlesource.com/|https://aosp.tuna.tsinghua.edu.cn/|g' fi   # Don't Delete .repo directory and hidden files #rm -rf $android_builddir/.??* ... Then save it and exit. # cd ~/ # source ~/ imx-o8.1.0_1.3.0_8m/imx_android_setup.sh Then android_build directory is created at ~/ # export MY_ANDROID=~/android_build          48 hours later: Compiling android8.1.0-1.3.0 BSP # cd ~/android_build # gedit ./prebuilts/sdk/tools/jack-admin               And find “JACK_SERVER_COMMAND” ,change it to be: JACK_SERVER_COMMAND="java -XX:MaxJavaStackTraceDepth=-1 -Djava.io.tmpdir=$TMPDIR $JACK_SERVER_VM_ARGUMENTS -Xmx4096m -cp $LAUNCHER_JAR $LAUNCHER_NAME"          Save and exit. And run: # ./prebuilts/sdk/tools/jack-admin stop-server # ./prebuilts/sdk/tools/jack-admin start-server # export ARCH=arm64 # export CROSS_COMPILE=~/android_build/prebuilts/gcc/linux-x86/aarch64/aarch64-linuxandroid-4.9/bin/aarch64-linux-android- # export LC_ALL=C # source build/envsetup.sh # lunch evk_8mq-userdebug               Begin to build android BSP for i.MX8MQ # make –j4 NXP TIC weidong sun 2018-08-15
View full article
Recently I published this i.MX Dev Blog post about the Gateworks plugin gst-variable-rtsp-server support for i.MX 6. Now, you can check how to use it on i.MX 8 SoCs as well. 1. Preparing the image In order to use gst-variable-rtsp-server plugin, prepare your machine and distro: Add the following line to conf/local.conf: IMAGE_INSTALL_append += "gstreamer1.0-rtsp-server gst-variable-rtsp-server" Download the attached patch and apply it by doing: $ cd <yocto_path>/sources/meta-fsl-bsp-release/ $ git am ~/Download/0001-Add-RTSP-support-for-i.MX-8-L4.14.78_ga1.0.0-or-olde.patch Note: This patch is not necessary for L4.14.98_ga2.0.0 BSP! Then, build the image with bitbake and deploy it to the SD card. 2. Video Test Source Example Server $ gst-variable-rtsp-server -p 9001 -u "videotestsrc ! v4l2h264enc ! rtph264pay name=pay0 pt=96" Client 2. Camera Example Server $ gst-variable-rtsp-server -p 9001 -u "v4l2src device=/dev/video0 ! video/x-raw,width=640,height=480 ! v4l2h264enc ! rtph264pay name=pay0 pt=96" Client In order to use VLC or other application as the client, just enter the URL as shown in the image below:
View full article
This document describes all the i.MX 8 MIPI-CSI use cases, showing the available cameras and daughter cards supported by the boards, the compatible Device Trees (DTS) files, and how to enable these different camera options on the i.MX 8 boards. Plus, this document describes some Advanced camera use cases too, such as multiples cameras output using imxcompositor_g2d plugin, GStreamer zero-copy pipelines and V4L2 API extra-controls examples.
View full article
i.mx8M evk board has HW decoder and SW encoder, this document introduce how to use HW decoder and SW encoder the bsp is the latest version L4.14.78, the environment is : $ DISTRO=fsl-imx-wayland MACHINE=imx8mqevk source fsl-setup-release.sh -b build-wayland $ bitbake fsl-image-validation-imx   For the 4.14.78, we don’t use mfgtool anymore, customer can use uuu.exe to program the image to the board, the uuu.exe can be found from https://github.com/NXPmicro/mfgtools/releases Here we use emmc as media, I attached the kerel_emmc.uuu for reference Open the cmd.exe, then use the command “uuu.exe kernel_emmc.uuu” to download the image to the emmc on the board as the picture shows When the board boot up, don’t forget to change the image and fdt_file as you want, for example, I use Image-imx8mqevk.bin as image name  and Image-fsl-imx8mq-evk.dtb as my fdt file, you can choose different image and fdt file as uuu file mentions. 1) Decoding   For play the video, we can use three solution to support this a) gplay-1.0 test.mp4 b) gst-launch-1.0 playbin uri=file:///mnt/sdcard/test.mp4 c) gst-launch-1.0 filesrc location=test.mp4 typefind=true ! video/quicktime ! aiurdemux ! queue max-size-time=0 ! vpudec ! autovideosink For play the two different video to the different display, current imx8M evk board supports dual hdmi output, in the uboot command: setenv fdt_file Image-fsl-imx8mq-evk-dual-display.dtb saveenv Use the command as below:    gst-launch-1.0 playbin uri=file:///test1.mp4 playbin uri=file:///test2.mp4 video-sink="glimagesink display-master=false display-slave=true" 2) Encoding Because imx8M evk don’t have hardware encoding, so we need to add the SW plugins in the bsp   a)add the commands as below in the /build/conf/local.conf "CORE_IMAGE-EXTRA_INSTALL += "gstreamer1.0-plugins-ugly-meta packagegroup-fsl-gsstreamer1.0-commercial gst-ffmpeg" LICENSE_FLAGS_WHITELIST = "commercial""        b)Create the new txt file and add “PACKAGECONFIG_mx8mq = "x264"”in the file        c)Rename the file as 0-plugins-ugly_%.bbappend and put this file under /sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-multimedia/gstreamer        d)Build the image you want, then download the new rootfs file in the board, use the command “gst-inspect-1.0 | grep x264”
View full article
Some of Chinese customer couldn’t normally download android source code from google site, here give a way to download android source from Mirror site of Tsinghua University. Preparations 1. Installing Ubuntu16.04.2 LTS Customer can download ubuntu-16.04.2-desktop-amd64.iso from https://www.ubuntu.com/download/desktop Then install it to VMware workstation player v12 or PC, after finishing installation, use “Software Update” to update system. In order to compile android9.0.0-2.0.0 BSP, necessary packages should also be installed on Ubuntu 16.04. $ sudo apt-get install gnupg $ sudo apt-get install flex $ sudo apt-get install bison $ sudo apt-get install gperf $ sudo apt-get install build-essential $ sudo apt-get install zip $ sudo apt-get install zlib1g-dev $ sudo apt-get install libc6-dev $ sudo apt-get install lib32ncurses5-dev $ sudo apt-get install x11proto-core-dev $ sudo apt-get install libx11-dev $ sudo apt-get install lib32z1-dev $ sudo apt-get install libgl1-mesa-dev $ sudo apt-get install tofrodos $ sudo apt-get install python-markdown $ sudo apt-get install libxml2-utils $ sudo apt-get install xsltproc $ sudo apt-get install uuid-dev:i386 liblzo2-dev:i386 $ sudo apt-get install gcc-multilib g++-multilib $ sudo apt-get install subversion $ sudo apt-get install openssh-server openssh-client $ sudo apt-get install uuid uuid-dev $ sudo apt-get install zlib1g-dev liblz-dev $ sudo apt-get install liblzo2-2 liblzo2-dev $ sudo apt-get install lzop $ sudo apt-get install git-core curl $ sudo apt-get install u-boot-tools $ sudo apt-get install mtd-utils $ sudo apt-get install android-tools-fsutils $ sudo apt-get install openjdk-8-jdk $ sudo apt-get install device-tree-compiler $ sudo apt-get install gdisk $ sudo apt-get install liblz4-tool $ sudo apt-get install m4 $ sudo apt-get install libz-dev More detail, see Android_User’s_Guide.pdf ( android 9.0.0-2.0.0 BSP documents) 2. Downloading and unpacking Android release package [ For android 9.0.0_2.2.0, see commemts, please!] https://www.nxp.com/support/developer-resources/evaluation-and-developmentboards/ sabre-development-system/android-os-for-i.mx-applicationsprocessors: IMXANDROID?tab=Design_Tools_Tab -- P9.0.0_2.0.0_GA_ANDROID_SOURCE File name is imx-p9.0.0_2.0.0-ga.tar.gz # cd ~ # tar xzvf imx-p9.0.0_2.0.0-ga.tar.gz Downloading Android 9.0.0-2.0.0 source code 1. Getting repo # cd ~ # mkdir bin # cd bin # curl https://mirrors.tuna.tsinghua.edu.cn/git/git-repo > ~/bin/repo # chmod a+x ~/bin/repo # export PATH=${PATH}:~/bin 2. Modifying repo File Open ~/bin/repo file with 'gedit' and Change google address From REPO_URL = 'https://gerrit.googlesource.com/git-repo' To REPO_URL = ' https://mirrors.tuna.tsinghua.edu.cn/git/git-repo/ ' 3、Setting email address # git config --global user.email "xxxx@nxp.com" # git config --global user.name "xxxx" [ Email & Name should be yours] 4、Modifying android setup script and Running it Open ~/imx-p9.0.0_2.0.0-ga/imx_android_setup.sh and add a line like below: ... ... if [ "$rc" != 0 ]; then echo "---------------------------------------------------" echo "-----Repo Init failure" echo "---------------------------------------------------" return 1 fi find -name 'aosp-p9.0.0_2.0.0-ga.xml'| \ xargs perl -pi -e 's|https://android.googlesource.com/|https://aosp.tuna.tsinghua.edu.cn/|g' fi ... ... Then save it and exit. # cd ~/ # source ~/imx-p9.0.0_2.0.0-ga/imx_android_setup.sh Then android_build directory is created at ~/ If fetching errors occur, like below, run “repo sync” again. # repo sync # export MY_ANDROID=~/android_build [Note] imx_android_setup.sh will be in charge of downloading all android source code. 5.Begin to compile android 9.0.0-2.0.0 BSP $ export ARCH=arm64 $ export CROSS_COMPILE=${MY_ANDROID}/prebuilts/gcc/linuxx86/aarch64/aarch64-linuxandroid-4.9/bin/aarch64-linux-android- $ cd ~/android_build/vendor $ cp -r ~/imx-p9.0.0_2.0.0-ga/vendor/* ./ $ cd ~/android_build $ source build/envsetup.sh $ lunch evk_8mm-userdebug $ make –j4 NXP TIC team Weidong sun 2019-05-05
View full article