i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
Attached is a chunk of the Filesystem needed to construct the Linux Image https://community.freescale.com/docs/DOC-93887
查看全文
Attached is a chunk of the Filesystem needed to construct the Linux Image https://community.freescale.com/docs/DOC-93887
查看全文
One chunk of the file system for the Linux Image i.MX 6Dual/6Quad Power Consumption Measurement Linux Image
查看全文
Attached is the Kernel image needed to construct the Linux Image i.MX 6Dual/6Quad Power Consumption Measurement Linux Image
查看全文
Attached is the Kernel needed to construct the following image: i.MX 6Dual/6Quad Power Consumption Measurement Linux Image
查看全文
Attached is the U-boot binary needed to construct the following image: i.MX 6Dual/6Quad Power Consumption Measurement Linux Image
查看全文
After upgrading Ubuntu 11.04 to 11.10, I encountered several building failures such as the following: error:"_FORTIFY_SOURCE" redefined [-Werror] To fix this building issue: 1. Following guides in Initializing a Build Environment | Android Open Source, to get build env ready for Ubuntu 11.10; 2. Edit build/core/combo/HOST_linux-x86.mk and replace:     "HOST_GLOBAL_CFLAGS += -D_FORTIFY_SOURCE=0"     with     "HOST_GLOBAL_CFLAGS += -U_FORTIFY_SOURCE -D_FORTIFY_SOURCE=0" Based on further Internet research, I found a Google Groups that summarizes all modifications to fix the building failure encountering in Ubuntu 11.10.
查看全文
1. Register to the meta-freescale maillist 2. Follow just the install and download steps indicated on the Freescale's github repo. Make sure you local code is in sync (repo sync) 3. Create a local branch using the repo command fs-community-bsp $ repo start <branch_name> --all      Where <branch_name> can be any name you want for your contribution (either a fix or a implementation) 4. Modify the files you want under the Freescale source folders (e.g. meta-fsl-arm) 5. Create a commit (follow the recommendations from Commit Patch Message Guidelines - Openembedded.org ) meta-fsl-arm $ git add <modified file 1> meta-fsl-arm $ git add <modified file 2> . . meta-fsl-arm $ git commit -m '<recipe name>: <my contribution>' 6. Create a patch file meta-fsl-arm $ git format-patch -s --subject-prefix='meta-fsl-arm][PATCH' -1 7. Configure ~./gitconfig so you are able to send e-mails through git, e.g. [sendemail]   smtpencryption = tls   smtpserver = smtp.gmail.com   smtpuser = [email protected]   smtpserverport = 587 8.Send the patch file to the community git send-email --to [email protected] <generated patch> 9. Check your patch's progress on meta-freescale mailing list. 10. In case you need to rework your patch, make sure you add v2 (version 2 of the patch) when creating the patch meta-fsl-arm $ git format-patch -s --subject-prefix='meta-fsl-arm][PATCH v2' -1
查看全文
Overview The purpose of this document is to provide the patches to fix display mess issue in TextView based on MX6 Android R13.4-GA and R13.4.1 ICS release. Please note these patches are only validated basically for dedicated issues. If you find any side effect with these patches, please add the comments into this document. Issue Description Software: R13.4-GA or R13.4.1 Android releases Hardware: i.MX6Dual/Quad SabreSD board or i.MX6DualLite SabreSD board. Test steps: Install testviewtest.apk Run this APK and key in the text, you will see the text display mess after key in more texts. You can also get the issue descriptions from https://community.freescale.com/thread/303194 Patches You can get the patches from attached textview_fix.zip. For R13.4-GA, please apply the following patches: kernel_imx, unzip Kernel/r13.4-ga/kernel-patch-r13.4-ga-gpu4.6.9p10.tar.gz and apply the patches. device/fsl-proprietary/gpu-viv: unzip gpu_lib/gpu-viv-lib-4.6.9p10-font-libGAL-crash-fix.tar.gz and replace lib folder. For R13.4.1, please apply the following patches: kernel_imx, Apply the patch Kernel/r13.4.1/0001-upgrade-gpu-4.6.9p10-kernel-driver_r13.4.1.patc device/fsl-proprietary/gpu-viv: unzip gpu_lib/gpu-viv-lib-4.6.9p10-font-libGAL-crash-fix.tar.gz and replace lib folder.
查看全文
Overview The purpose of this document is to demonstrate how to enable USB Bluetooth Dongle based on i.MX6 Android ICS. Hardware i.MX6Dual/Quad or i.MX6DualLite SabreSD board USB Bluetooth Dongle Software i.MX6DQ/MX6DL Android ICS R13.4 or R13.4.1 Release Changes 0001-enable-usb-dongle-BT.patch: Update bluedroid to disable RFKILL and enable HCIATTACH property for USB Bluetooth Dongle. diff --git a/bluedroid/Android.mk b/bluedroid/Android.mk index 17df49b..569be44 100644 --- a/bluedroid/Android.mk +++ b/bluedroid/Android.mk @@ -5,6 +5,13 @@ LOCAL_PATH:= $(call my-dir) include $(CLEAR_VARS) +ifeq ($(BOARD_BLUETOOTH_DOES_NOT_USE_RFKILL),true) +  LOCAL_CFLAGS := $(LOCAL_CFLAGS) -DBLUETOOTH_DOES_NOT_USE_RFKILL +endif + +ifeq ($(BOARD_BLUETOOTH_USES_HCIATTACH_PROPERTY),true) +  LOCAL_CFLAGS := $(LOCAL_CFLAGS) -DBLUETOOTH_HCIATTACH_USING_PROPERTY +endif LOCAL_SRC_FILES := \   bluetooth.c diff --git a/bluedroid/bluetooth.c b/bluedroid/bluetooth.c index 4cc9204..2636942 100644 --- a/bluedroid/bluetooth.c +++ b/bluedroid/bluetooth.c @@ -44,7 +44,7 @@ static int rfkill_id = -1; static char *rfkill_state_path = NULL; - +#ifndef BLUETOOTH_DOES_NOT_USE_RFKILL static int init_rfkill() {      char path[64];      char buf[16]; @@ -135,6 +135,7 @@ out:      if (fd >= 0) close(fd);      return ret; } +#endif static inline int create_hci_sock() {      int sk = socket(AF_BLUETOOTH, SOCK_RAW, BTPROTO_HCI); @@ -151,13 +152,20 @@ int bt_enable() {      int ret = -1;      int hci_sock = -1;      int attempt; - +#ifndef BLUETOOTH_DOES_NOT_USE_RFKILL      if (set_bluetooth_power(1) < 0) goto out; - +#endif +#ifndef BLUETOOTH_HCIATTACH_USING_PROPERTY      LOGI("Starting hciattach daemon"); -    if (property_set("ctl.start", "hciattach") < 0) { +    if (property_set("ctl.start", "hciattach") < 0) +#else +    if (property_set("bluetooth.hciattach", "true") < 0) +#endif +    {          LOGE("Failed to start hciattach"); +#ifndef BLUETOOTH_DOES_NOT_USE_RFKILL          set_bluetooth_power(0); +#endif          goto out;      } @@ -186,14 +194,18 @@ int bt_enable() {          if (property_set("ctl.stop", "hciattach") < 0) {              LOGE("Error stopping hciattach");          } +#ifndef BLUETOOTH_DOES_NOT_USE_RFKILL          set_bluetooth_power(0); +#endif          goto out;      }      LOGI("Starting bluetoothd deamon");      if (property_set("ctl.start", "bluetoothd") < 0) {          LOGE("Failed to start bluetoothd"); +#ifndef BLUETOOTH_DOES_NOT_USE_RFKILL          set_bluetooth_power(0); +#endif          goto out;      } @@ -222,14 +234,20 @@ int bt_disable() {      ioctl(hci_sock, HCIDEVDOWN, HCI_DEV_ID);      LOGI("Stopping hciattach deamon"); -    if (property_set("ctl.stop", "hciattach") < 0) { +#ifndef BLUETOOTH_HCIATTACH_USING_PROPERTY +    if (property_set("ctl.stop", "hciattach") < 0) +#else +   if (property_set("bluetooth.hciattach", "false") < 0) +#endif +   {          LOGE("Error stopping hciattach");          goto out;      } - +#ifndef BLUETOOTH_DOES_NOT_USE_RFKILL      if (set_bluetooth_power(0) < 0) {          goto out;      } +#endif      ret = 0; out: @@ -246,9 +264,10 @@ int bt_is_enabled() {      // Check power first +#ifndef BLUETOOTH_DOES_NOT_USE_RFKILL      ret = check_bluetooth_power();      if (ret == -1 || ret == 0) goto out; - +#endif      ret = -1;      // Power is on, now check if the HCI interface is up 0002-usb_dongle-on-SabreSD.patch: Update MX6 board configuration files to enable USB Bluetooth dongle feature. diff --git a/imx6/imx6.mk b/imx6/imx6.mk @@ -63,6 +63,7 @@ PRODUCT_PACKAGES += \ PRODUCT_PACKAGES += \   audio.tinyalsa.freescale   \   audio.legacy.freescale    \ +        audio.a2dp.default                      \   alsa_aplay                \   alsa_arecord    \   alsa_amixer        \ diff --git a/imx6/sabresd/SabreSDBoardConfigComm.mk b/imx6/sabresd/SabreSDBoardConfigComm.mk index 03d8ce5..1a8a6bd 100755 --- a/imx6/sabresd/SabreSDBoardConfigComm.mk +++ b/imx6/sabresd/SabreSDBoardConfigComm.mk -# atheros 3k BT -BOARD_USE_AR3K_BLUETOOTH := true +# Default use USB BT dongle for imx6, so should enable below +BOARD_BLUETOOTH_DOES_NOT_USE_RFKILL := true +BOARD_BLUETOOTH_USES_HCIATTACH_PROPERTY := true + USE_ION_ALLOCATOR := false USE_GPU_ALLOCATOR := true diff --git a/imx6/sabresd/init.rc b/imx6/sabresd/init.rc index ff9f0ff..f127177 100755 --- a/imx6/sabresd/init.rc +++ b/imx6/sabresd/init.rc @@ -84,9 +84,12 @@ on boot      # No bluetooth hardware present      setprop hw.bluetooth 0      setprop wlan.interface wlan0 +    setprop hw.bluetooth 1 diff --git a/imx6/sabresd/required_hardware.xml b/imx6/sabresd/required_hardware.xml index c9a2271..f7db37b 100644 --- a/imx6/sabresd/required_hardware.xml +++ b/imx6/sabresd/required_hardware.xml @@ -22,6 +22,7 @@      <feature name="android.hardware.camera.flash" />      <feature name="android.hardware.camera.front" />      <feature name="android.hardware.location" /> +    <feature name="android.hardware.bluetooth" />      <feature name="android.hardware.location.network" />      <feature name="android.hardware.location.gps" />      <feature name="android.hardware.telephony" />
查看全文
The i.MX6Q-SDP is used to stream OV5642 parallel camera video encoded as JPEG using the hardware CODEC engine to a Linux client which decodes and displays on the screen.
查看全文
Abstract This is a small tutorial about running a simple OpenCL application in an i.MX6Q. It covers a very small introduction to OpenCL, the explanation of the code and how to compile and run it.   Requirements   Any i.MX6Q board. Linux BSP with the gpu-viv-bin-mx6q package (for instructions on how to build the BSP, check the BSP Users Guide)   OpenCL overview   OpenCL allows any program to use the GPGPU features of the GC2000 (General-Purpose Computing on Graphics Processing Units) that means to use the i.MX6Q GPU processing power in any program.   OpenCL uses kernels which are functions that can be executed in the GPU. These functions must be written in a C99 like code. In our current GPU there is no scheduling so each kernel will execute in a FIFO fashion. iMx6Q GPU is OpenCL 1.1 EP conformant. The Code   The example provided here performs a simple addition of arrays in the GPU. The header needed to use openCL is cl.h and is under /usr/include/CL in your BSP rootfs when you install the gpu-viv-bin-mx6q package. The header is typically included like this: #include <CL/cl.h> The libraries needed to link the program are libGAL.so and libOpenCL.so those are under /usr/lib in your BSP rootfs.   For details on the OpenCL API check the khronos page: http://www.khronos.org/opencl/ Our kernel source is as follows: __kernel void VectorAdd(__global int* c, __global int* a,__global int* b) {      // Index of the elements to add      unsigned int n = get_global_id(0);      // Sum the nth element of vectors a and b and store in c      c[n] = a[n] + b[n]; } The kernel is declared with the signature     __kernel void VectorAdd(__global int* c, __global int* a,__global int* b).   This takes vectors a and b as arguments adds them and stores the result in the vector c. It looks like a normal C99 method except for the keywords kernel and global. kernel tells the compiler this function is a kernel, global tells the compiler this attributes are of global address space. get_global_id built-in function   This function will tell us to which index of the vector this kernel corresponds to. And in the last line the vectors are added. Below is the full source code commented. //************************************************************ // Demo OpenCL application to compute a simple vector addition // computation between 2 arrays on the GPU // ************************************************************ #include <stdio.h> #include <stdlib.h> #include <CL/cl.h> // // OpenCL source code const char* OpenCLSource[] = { "__kernel void VectorAdd(__global int* c, __global int* a,__global int* b)", "{", " // Index of the elements to add \n", " unsigned int n = get_global_id(0);", " // Sum the nth element of vectors a and b and store in c \n", " c[n] = a[n] + b[n];", "}" }; // Some interesting data for the vectors int InitialData1[20] = {37,50,54,50,56,0,43,43,74,71,32,36,16,43,56,100,50,25,15,17}; int InitialData2[20] = {35,51,54,58,55,32,36,69,27,39,35,40,16,44,55,14,58,75,18,15}; // Number of elements in the vectors to be added #define SIZE 100 // Main function // ************************************************************ int main(int argc, char **argv) {      // Two integer source vectors in Host memory      int HostVector1[SIZE], HostVector2[SIZE];      //Output Vector      int HostOutputVector[SIZE];      // Initialize with some interesting repeating data      for(int c = 0; c < SIZE; c++)      {           HostVector1[c] = InitialData1[c%20];           HostVector2[c] = InitialData2[c%20];           HostOutputVector[c] = 0;      }      //Get an OpenCL platform      cl_platform_id cpPlatform;      clGetPlatformIDs(1, &cpPlatform, NULL);      // Get a GPU device      cl_device_id cdDevice;      clGetDeviceIDs(cpPlatform, CL_DEVICE_TYPE_GPU, 1, &cdDevice, NULL);      char cBuffer[1024];      clGetDeviceInfo(cdDevice, CL_DEVICE_NAME, sizeof(cBuffer), &cBuffer, NULL);      printf("CL_DEVICE_NAME: %s\n", cBuffer);      clGetDeviceInfo(cdDevice, CL_DRIVER_VERSION, sizeof(cBuffer), &cBuffer, NULL);      printf("CL_DRIVER_VERSION: %s\n\n", cBuffer);      // Create a context to run OpenCL enabled GPU      cl_context GPUContext = clCreateContextFromType(0, CL_DEVICE_TYPE_GPU, NULL, NULL, NULL);      // Create a command-queue on the GPU device      cl_command_queue cqCommandQueue = clCreateCommandQueue(GPUContext, cdDevice, 0, NULL);      // Allocate GPU memory for source vectors AND initialize from CPU memory      cl_mem GPUVector1 = clCreateBuffer(GPUContext, CL_MEM_READ_ONLY |      CL_MEM_COPY_HOST_PTR, sizeof(int) * SIZE, HostVector1, NULL);      cl_mem GPUVector2 = clCreateBuffer(GPUContext, CL_MEM_READ_ONLY |      CL_MEM_COPY_HOST_PTR, sizeof(int) * SIZE, HostVector2, NULL);      // Allocate output memory on GPU      cl_mem GPUOutputVector = clCreateBuffer(GPUContext, CL_MEM_WRITE_ONLY,      sizeof(int) * SIZE, NULL, NULL);      // Create OpenCL program with source code      cl_program OpenCLProgram = clCreateProgramWithSource(GPUContext, 7, OpenCLSource, NULL, NULL);      // Build the program (OpenCL JIT compilation)      clBuildProgram(OpenCLProgram, 0, NULL, NULL, NULL, NULL);      // Create a handle to the compiled OpenCL function (Kernel)      cl_kernel OpenCLVectorAdd = clCreateKernel(OpenCLProgram, "VectorAdd", NULL);      // In the next step we associate the GPU memory with the Kernel arguments      clSetKernelArg(OpenCLVectorAdd, 0, sizeof(cl_mem), (void*)&GPUOutputVector);      clSetKernelArg(OpenCLVectorAdd, 1, sizeof(cl_mem), (void*)&GPUVector1);      clSetKernelArg(OpenCLVectorAdd, 2, sizeof(cl_mem), (void*)&GPUVector2);      // Launch the Kernel on the GPU      // This kernel only uses global data      size_t WorkSize[1] = {SIZE}; // one dimensional Range      clEnqueueNDRangeKernel(cqCommandQueue, OpenCLVectorAdd, 1, NULL,      WorkSize, NULL, 0, NULL, NULL);      // Copy the output in GPU memory back to CPU memory      clEnqueueReadBuffer(cqCommandQueue, GPUOutputVector, CL_TRUE, 0,      SIZE * sizeof(int), HostOutputVector, 0, NULL, NULL);      // Cleanup      clReleaseKernel(OpenCLVectorAdd);      clReleaseProgram(OpenCLProgram);      clReleaseCommandQueue(cqCommandQueue);      clReleaseContext(GPUContext);      clReleaseMemObject(GPUVector1);      clReleaseMemObject(GPUVector2);      clReleaseMemObject(GPUOutputVector);      for( int i =0 ; i < SIZE; i++)           printf("[%d + %d = %d]\n",HostVector1[i], HostVector2[i], HostOutputVector[i]);      return 0; } How to compile in Host   Get to your ltib folder and run $./ltib m shell This way you will be using the cross compiler ltib uses and the default include and lib directories will be the ones in your bsp. Then run LTIB> gcc cl_sample.c -lGAL -lOpenCL -o cl_sample. How to run in the i.MX6Q   Insert the GPU module root@freescale/home/user $ modprobe galcore Copy the compiled CL program and then run root@freescale /home/user$ ./cl_sample References   [1] ttp://www.khronos.org/opencl/ Original Attachment has been moved to: libOpenCL.so.zip Original Attachment has been moved to: libCLC_Android.so.zip Original Attachment has been moved to: libOpenCL_Android.so.zip Original Attachment has been moved to: libCLC.so.zip
查看全文
Issue Description When running Android R10.4 on MX51 BBG, the system can not resume sometimes by following the test steps: 1) Enable CLAA-WVGA lcd panel - single display. 2) Play a video in Gallery. 3) Press power key to suspend the system. 4) Press power key to resume the system. 5) Do 3) and 4) continuously. Debug Details When adding the following debug information into vpu_resume function in file drivers/mxc/vpu/mxc_vpu.c, the system gets hang into while loop with the log "VPU Blocking 1**************": static int vpu_resume(struct platform_device *pdev) {         int i;                 WRITE_REG(BITVAL_PIC_RUN, BIT_INT_ENABLE);                 WRITE_REG(0x1, BIT_BUSY_FLAG);                 WRITE_REG(0x1, BIT_CODE_RUN);                 while (READ_REG(BIT_BUSY_FLAG)) {                           printk("VPU Blocking 1**************\r\n");                }; } Root Cause In some use cases,  VPU power gating didn't happen after vpu_suspend() returned successfully because some other devices refused to suspend or other reasons. So vpu_resume() ran FW init code when VPU was idle instead of power off, which could keep BIT_BUSY_FLAG always be 1. Solution In vpu_resume(), if VPU PC is not 0, which means VPU is still running, skip running FW init code. See attached patch based on R10.4.
查看全文
Overview This purpose of this document is to introduce how to support recovery mode for POR reboot event based on MX6 Android R13.4.1. Background If you boot Android R13.4.1 on MX6 SabreSD board, the reboot reason is Watchdog. But if the reboot reason is changed from Watchdog to POR, the recovery mode is failed to enter after factory reset. In R13.4.1, the bit 8 of SRC_GPR10 is used as the persistent bit of recovery mode. This bit is expected to be kept after reboot so that U-boot can use this bit to distinguish what mode should enter. However all SRC registers will be reset on POR sequence according to i.MX6DQRM Section 59.4.1.2.3 IPP_RESET_B (POR). So when the reboot reason is POR, the persistent bit of recovery mode is cleared even if the software set it before reboot. It causes the bootloader won't enter recovery mode after reboot. Software Changes According to i.MX6DQRM, the SNVS_LP General Purpose Register provides a 32 bit read write register, which can be used by any application for retaining 32 bit data during a power-down mode. So to support recovery mode for POR event, the SNVS_LP register can be used to store the persistent bit of recovery mode. The following changes are reqiured to apply (See patches.tar.gz) Apply for Uboot patch bootable/bootloader/uboot-imx/0001-ENGR00235817-mx6-use-SNVS-LPGPR-register-to-store-bo.patch. diff --git a/cpu/arm_cortexa8/mx6/generic.c b/cpu/arm_cortexa8/mx6/generic.c index 257c930..bd47130 100644 --- a/cpu/arm_cortexa8/mx6/generic.c +++ b/cpu/arm_cortexa8/mx6/generic.c @@ -1146,14 +1146,14 @@ int check_and_clean_recovery_flag(void) {   int flag_set = 0;   u32 reg; - reg = readl(SRC_BASE_ADDR + SRC_GPR10); + reg = readl(SNVS_BASE_ADDR + SNVS_LPGPR);   flag_set = !!(reg & ANDROID_RECOVERY_BOOT);   /* clean it in case looping infinite here.... */   if (flag_set) {    reg &= ~ANDROID_RECOVERY_BOOT; -  writel(reg, SRC_BASE_ADDR + SRC_GPR10); +  writel(reg, SNVS_BASE_ADDR + SNVS_LPGPR);   }   return flag_set; @@ -1168,14 +1168,15 @@ int fastboot_check_and_clean_flag(void) {   int flag_set = 0;   u32 reg; - reg = readl(SRC_BASE_ADDR + SRC_GPR10); + + reg = readl(SNVS_BASE_ADDR + SNVS_LPGPR);   flag_set = !!(reg & ANDROID_FASTBOOT_BOOT);   /* clean it in case looping infinite here.... */   if (flag_set) {    reg &= ~ANDROID_FASTBOOT_BOOT; -  writel(reg, SRC_BASE_ADDR + SRC_GPR10); +  writel(reg, SNVS_BASE_ADDR + SNVS_LPGPR);   }   return flag_set; diff --git a/include/asm-arm/arch-mx6/mx6.h b/include/asm-arm/arch-mx6/mx6.h index efb90c2..45381e2 100644 --- a/include/asm-arm/arch-mx6/mx6.h +++ b/include/asm-arm/arch-mx6/mx6.h @@ -732,6 +732,8 @@ #define SRC_GPR9  0x40 #define SRC_GPR10  0x44 +#define SNVS_LPGPR              0x68 + /* Get Board ID */ #define board_is_rev(system_rev, rev) (((system_rev & 0x0F00) == rev) ? 1 : 0) #define chip_is_type(system_rev, rev) \ Apply for kernel patch kernel_imx/0001-ENGR00235817-mx6-use-SNVS-LPGPR-register-to-store-bo.patch diff --git a/arch/arm/mach-mx6/system.c b/arch/arm/mach-mx6/system.c index 6d24f22..61649c5 100644 --- a/arch/arm/mach-mx6/system.c +++ b/arch/arm/mach-mx6/system.c @@ -563,7 +563,7 @@ void mxc_clear_mfgmode(void) #endif #ifdef CONFIG_MXC_REBOOT_ANDROID_CMD -/* This function will set a bit on SRC_GPR10[7-8] bits to enter +/* This function will set a bit on SNVS_LPGPR[7-8] bits to enter   * special boot mode.  These bits will not clear by watchdog reset, so   * it can be checked by bootloader to choose enter different mode.*/ @@ -574,18 +574,18 @@ void do_switch_recovery(void) {   u32 reg; - reg = __raw_readl(SRC_BASE_ADDR + SRC_GPR10); + reg = __raw_readl(MX6Q_SNVS_BASE_ADDR + SNVS_LPGPR);   reg |= ANDROID_RECOVERY_BOOT; - __raw_writel(reg, SRC_BASE_ADDR + SRC_GPR10); + __raw_writel(reg, MX6Q_SNVS_BASE_ADDR + SNVS_LPGPR); } void do_switch_fastboot(void) {   u32 reg; - reg = __raw_readl(SRC_BASE_ADDR + SRC_GPR10); + reg = __raw_readl(MX6Q_SNVS_BASE_ADDR + SNVS_LPGPR);   reg |= ANDROID_FASTBOOT_BOOT; - __raw_writel(reg, SRC_BASE_ADDR + SRC_GPR10); + __raw_writel(reg, MX6Q_SNVS_BASE_ADDR + SNVS_LPGPR); } #endif diff --git a/arch/arm/plat-mxc/include/mach/mx6.h b/arch/arm/plat-mxc/include/mach/mx6.h index 48b04b1..bb22de0 100644 --- a/arch/arm/plat-mxc/include/mach/mx6.h +++ b/arch/arm/plat-mxc/include/mach/mx6.h @@ -302,6 +302,8 @@ #define SRC_GPR9   0x40 #define SRC_GPR10   0x44 +#define SNVS_LPGPR   0x68 + /* GPC offsets */ #define MXC_GPC_CNTR_OFFSET  0x0
查看全文
Overview i.MX6Dual/Quad and i.MX6DualLite supports 32-bit and 64-bit DDR3. Freescale i.MX6 SabreSD board deploys 64bit DDR3 and 64bit DDR3 script is delivered into Linux/Android Software release. This document introduces how to create i.MX6 32bit DDR script based on 64bit DDR script when deploying 32bit DDR on customized board. Changes Set the DSE field in the following iomux registers to 0 - disable unused IO pad to save power: IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS4 IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS5 IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS6 IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS7 IOMUXC_SW_PAD_CTL_GRP_B4DS IOMUXC_SW_PAD_CTL_GRP_B5DS IOMUXC_SW_PAD_CTL_GRP_B6DS IOMUXC_SW_PAD_CTL_GRP_B7DS IOMUXC_SW_PAD_CTL_PAD_DRAM_DQM4 IOMUXC_SW_PAD_CTL_PAD_DRAM_DQM5 IOMUXC_SW_PAD_CTL_PAD_DRAM_DQM6 IOMUXC_SW_PAD_CTL_PAD_DRAM_DQM7 Update MMDC registers to reflect 32bit DDR changes: MMDC0_MDASP: Update CS0_END if CS size is changed. MMDC0_MDCTL: set DSIZ to 32 bit MMDC1_MPODTCTRL: Set it as 0 and disable the odt of higher byte Follow "i.MX 6 Series DDR Calibration" Application note to calibrate DDR parameters. Reference One example about 32bit DDR script is located under uboot-imx git ( File: board/freescale/mx6q_sabresd/flash_header.S). Open it and you can see the following script: #if defined CONFIG_MX6DL_DDR3 #if defined CONFIG_DDR_32BIT ... #endif You can refer to it and create your 32bit DDR script.
查看全文
Starting from $52, the VAR-SOM-MX6 sets the bar for unparalleled design flexibility. The VAR-SOM-MX6 ensures scalable and simplified development, while also extending the product lifecycle. Thanks to four CPU core assembly options, customers can apply a single System on Module in a broad range of applications to achieve short time-to-market for their current innovations, while still accommodating potential R&D directions and marketing opportunities.     VAR-SOM-MX6 CPU: Freescale iMX6 Key features include: Freescale i.MX6 1.2GHz Quad / Dual / Single core Cortex-A9       2GB DDR3, 1GB SLC NAND Flash       Full HD 1080p video encoding/decoding capability       Vivante GPU providing 2D/3D acceleration       Simultaneous multiple display support       Gigabit Ethernet       TI WiLink™ 6.0 single-chip connectivity solution (Wi-Fi, Bluetooth®)       PCI-Express 2.0, S-ATA 3.0       Camera interface       USB 2.0: Host, OTG       Audio In/Out       Dual CAN Bus This versatile solution's -40 to 85°C temperature range and Dual CAN support is ideal for industrial applications, while 1080p video and graphics accelerations make it equally suitable for intensive multimedia applications. The impressive scalability of the VAR-SOM-MX6 satisfies the needs of the most demanding future application requirements whether faster processing power, enhanced algorithms or improved graphics and video performance to name just a few. The VAR-SOM-MX6 is an all-round solution with broad connectivity and sophisticated video and acceleration graphic capabilities, delivering a range of middle to high end assembly options all from the same product. For more details, please see VAR-SOM-MX6 CPU: Freescale iMX6
查看全文
The attached patch applies to iMX6_Platform_SDK for i.MX6 Dual and Quad and brings 2 additional SDMA memory to memory scripts: fixed destination address, increasing source address fixed source address, increasing destination address. With this patch, the new scripts are also integrated in the SDMA Test menu of the Platform SDK. I created these scripts starting from the ROM script ap_to_ap. In order to dump the content of the SDMA ROM, I used mxc_printSDMAcontext function which is also included in the attached patch and can be invoked when needed.
查看全文
Apply this patch into the LTIB folder.
查看全文
Some i.MX25 customers reported an issue for the GPT timer, when using 120MHz (240MHz UPLL divided 2) clock source as the GPT per_clk, the timer will not be increased all the time in free-run mode. If using 66.5MHz IPG clock and 133MHz PER clock as the clock source, there are no such issue. There are 4 test cases in the attached test code. Case 0: in CCM_MCR, set bit 5 as 0 for 133MHz HCLK as the gpt_per_clk source;  in GPT_CR bit[8:6], set 0b001 ipg_clk (66.5MHz). There is no issue, the GPT counter is fixed at 4 between old_cnt and new_cnt. Case 1: in CCM_MCR, set bit 5 as 0 for 133MHz HCLK as the gpt_per_clk source;  in GPT_CR bit[8:6], set 0b010 ipg_clk_highfreq (133MHz). There is no issue, the GPT counter is fixed at 8 between old_cnt and new_cnt. Case 2: in CCM_MCR, set bit 5 as 1 for 240MHz UPLL divided by 2 as the gpt_per_clk source;  in GPT_CR bit[8:6], set 0b001 ipg_clk (60MHz). There is no issue, the GPT counter is fixed at 4 between old_cnt and new_cnt. Case 3: in CCM_MCR, set bit 5 as 0 for 240MHz UPLL divided by 2 as the gpt_per_clk source;  in GPT_CR bit[8:6], set 0b010 ipg_clk_highfreq (120MHz). There is issue, the GPT counter is not a fixed value between old_cnt and new_cnt, and sometimes it will be negative. Count 9874: 4 old_cnt: 0x188849dc new_cnt: 0x188849e0 Count 9877: 12 old_cnt: 0x18918400 new_cnt: 0x1891840c Count 9915: 4 old_cnt: 0x189aea90 new_cnt: 0x189aea94 Count 9937: -12 old_cnt: 0x18a42458 new_cnt: 0x18a4244c Count 9967: 4 old_cnt: 0x18adb17c new_cnt: 0x18adb180 In fact, it is not an issue, when using UPLL as the GPT clock source, the maxim frequency should be 60MHz. That's why all other three test case is OK and it only failed on this case.
查看全文
In L2.6.35_11.09.01_ER BSP Uboot, the MMC driver was updated, but there is issue that when you modified some uboot code, the MMC driver has chance to fail to work. The root cause is that mmc->has_init hasn't been initialized. Sometimes the value will be not zero, then mmc driver will be skipped for initialization. Attached is the patch to fix this issue in L2.6.35_11.09.01_ER BSP Uboot.
查看全文