i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
Hello, here Jorge. On this post I will explain how to configure, record and play audio using an i.MX 8MIC-RPI-MX8 Board. Requirements: I.MX 8M Mini EVK Linux Binary Demo Files - i.MX 8MMini EVK (L5.15.52_2.1.0) i.MX 8MIC-RPI-MX8 Board Serial console emulator (Tera Term, Putty, etc.) Headphones/speakers The 8MIC-RPI-MX8 accessory board is designed for voice enabled application prototyping and development on the i.MX 8M family. The board plugs directly into the 40-pin expansion connector on the i.MX 8M Mini and Nano EVK’s. Some features about this board are: 8 PDM Microphones 8 monochrome LEDs 4 multi-color LEDs 2 status LEDs 4 pushbuttons Microphone Mute Switch Microphone geometry switch Connecting the i.MX 8MIC-RPI-MX8 Board. The i.MX 8MIC-RPI-MX8 Board has a 40-pin expansion connector that you can plug it directly to the EVK board. Ensure that pin 1 of the 8MIC-RPI-MX8 is aligned with pin 1 on the EVK J1001 as is showed on the next figure:  Selecting the device tree on the board. Once the pre-compiled image is flashed on the board (Flashing Linux BSP using UUU) and you connected the 8MIC-RPI-MX8 it is necessary to select the correct device tree to handle 8MIC board. On U-boot check the available .dtb files on the BSP using the next command: u-boot=> fatls mmc 2:1 And you will get the corresponding list of .dbt files:  On this case we are working with an I.MX 8M Mini EVK and the corresponding .dtb file is: imx8mm-evk-8mic-revE.dtb To select it you need to set the environment variable and save it with: u-boot=> setenv fdtfile imx8mm-evk-8mic-revE.dtb u-boot=> saveenv Doble check it using: u-boot=> printenv fdtfile   Now it is time to boot Linux using the next command: u-boot=> boot Recording audio with the i.MX 8MIC-RPI-MX8 Board. The Advanced Linux Sound Architecture (ALSA) provides audio and MIDI functionality to the Linux operating system. ALSA has the following significant features: Efficient support for all types of audio interfaces, from consumer sound cards to professional multichannel audio interfaces. Fully modularized sound drivers. SMP and thread-safe design. User space library (alsa-lib) to simplify application programming and provide higher level functionality. Support for the older Open Sound System (OSS) API, providing binary compatibility for most OSS programs. Once we are on Linux, we can check our audio codecs detected on the board using: arecord -l   Now, to record audio we need to use the ALSA arecord command to start recording with IMX8 boards, there are different options that you can check on the next link. On this case we are going to use the next: arecord -D hw:imxaudiomicfil -c8 -f s16_le -r48000 -d10 sample.wav -D: selects the device. -c: selects the number of channels on the recording. -f: selects the format. -r: selects the sample rate. -d: determinate the duration recording time in seconds. sample.wav: Is the name of the resulting audio file. Running the last command, we started to record audio. It is time to make some noise and record it!   Playing audio from IMX8 boards. Now it is time to connect our headphones or speakers to the jack.   Also, as on arecord command you can check the devices where you can play audio from the board using the next command: aplay -l And you will get all the codecs to play audio:   To play our recordings we need to use the ALSA aplay command, it is important to select the correct audio codec to hear the audio from the jack on the board: aplay -Dplughw:3,0 sample.wav -D: selects the device. sample.wav: Is the name of audio file to play   Hope this will helpful for people who wants to record audio using PDM microphones and playing audio from IMX8 boards. Best regards.
View full article
On behalf of Gopise Yuan. A collection of several GST debugging tips and known-how. When you need to play onto a DRM layer/plane directly without going through compositor, kmssink should be a good choice: // kmssink, with scale and adjust alpha property (opaque) and zpos (this requires kmssink>=1.16): gst-launch-1.0 filesrc location=/media/AVC-AAC-720P-3M_Alan.mov ! decodebin ! imxvideoconvert_g2d ! kmssink plane-id=37 render-rectangle="<100,100,720,480>" can-scale=false plane-properties=s,alpha=65535,zpos=2 When using playbin, you can still customize the pipeline besides the sink plugin, e.g. add a converter plugin: // Playbin with additional customization on converter before sink: gst-launch-1.0 playbin uri=file:///mnt/MP4_H264_AAC_1920x1080.mp4 video-sink="imxvideoconvert_g2d ! video/x-raw,format=BGRA,width=1920,height=1080 ! kmssink plane-id=44" GST can generate a pipeline graph for analyzing the pipeline in a intuitive manner: // Generate pipeline graph: 1. Export GST_DEBUG_DUMP_DOT_DIR=<dump-folder>, GST_DEBUG=4 2. Run pipeline with gst-launch or others. 3. Copy all dump files (.dot) from <dump-folder>. Note: one dump file will be created for each state transaction. Normally, what we need will be PAUSE_READY or READY_PAUSE, after which pipeline has been setup. 4. Convert the .dot file to PDF with Graphviz: dot -Tpdf 0.00.03.685443250-gst-launch.PAUSED_READY.dot > pipeline_PAUSED_READY.pdf  
View full article
1. Intro   This document contains instructions to run run the SAI low power audio demo on the i.MX 8M Plus EVK. Here, the  RPSMG to allows audio to be passed from the A53 cluster running Linux to the M7 core. The latter controls the on board WM8960 audio codec,  which is connected to a 3.5 mm audio jack that allow us to play music using headphones. I will show the necessary steps to make the demo work and will add some GStreamer examples to demonstrate the demo's capabilities.   TBD: update this with a nice diagram that depicts the A53 and M7 RPMSG channel. 2. Requirements   Hardware  MX 8M Plus EVK Headphones with 3.5 mm audio jack Type-C power supply for i.MX 8M Plus EVK Micro USB to USB adapter cable Software  A recent prebuilt Linux BSP image from NXP.com ( we tested this on 5.15.35 and 5.15.5 releases) Windows 10 or Ubuntu 20.04 Workstation MCUXpresso SDK for i.MX 8M Plus ( available from:  Welcome | MCUXpresso SDK Builder (nxp.com)) 3. Reference documentation for this example   MCUXpresso SDK   [1] Getting Started with MCUXpresso SDK for EVK-MIMX8MP     Available within the MCUXpresso SDK package:  \{INSTALL PATH}\SDK_X_X_X_EVK-MIMX8MP\docs    [2] SAI low power audio README file Contains instructions for the SAI Low Power Audio Demo.  Available within the MCUXpresso SDK package: \{INSTALL PATH}\SDK_X_X_X_EVK-MIMX8MP\boards\evkmimx8mp\demo_apps\sai_low_power_audio   4. Downloading a pre-built Linux BSP image for the i.MX 8M Plus   I will make use of the prebuilt Linux Image for the i.MX 8M Plus EVK for demonstrating the demo works.  At the moment of writing this time, I used the 5.15.32 release, although there are older releases like 5.10.5 that I tested and proved to work with no issues. This SAI Low Power Audio Demo shall work for other processors on the i.MX 8M family. Although specific instructions ( e.g. load address for M-core binary load) might require some adaptation. For M-core load address, please refer to the specific MCUXpresso SDK documentation for each processor. The prebuilt Linux image (5.15.32) for the i.MX 8M Plus EVK can be downloaded from here: https://www.nxp.com/webapp/Download?colCode=L5.15.32_2.0.0_MX8MP&appType=license You can download other releases from here: Embedded Linux for i.MX Applications Processors | NXP Semiconductors . Select a version and a board and select download. 5. Flashing the BSP image   If you are using an Ubuntu 20.04 workstation, I recommend you to flash the image using dd. For this, you can refer to the i.MX Linux User's Guide: Section - 4.3.2 Copying the full SD card image - https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf sudo dd if=.wic of=/dev/sdx bs=1M && sync NOTE: when using dd, ALWAYS, double check the of device that you are about to writing. Messing up with another location or partition will harm your system   If you are following this document on a Windows machine: You can use the Universal Update Utility (UUU) to flash your image on either the board's eMMC or SD card. Document named UUU.pdf shall serve as your reference guide for further instructions and flashing examples. It is available along with UUU binary here: https://github.com/NXPmicro/mfgtools/releases Two examples are shown below for your convenience:                                     SD card flash                                                 uuu -b sd_all bootloader rootfs.sdcard.bz2                                     eMMC flash                                                 uuu -b emmc_all bootloader rootfs.sdcard.bz2        uuu uuu.auto NOTE: UUU is also compatible with Ubuntu NOTE: there are other engineers who like to use BalenaEtcher for flashing their BSP images. I have tested it and works on both Ubuntu and Windows 10 machines.   6. Preparing the BSP and booting up M7 core  using U-Boot   I am writing this upon the instructions contained on the README file for the low power audio example  [2]. Instructions ready to copy and paste will follow:   Instruct U-Boot to pass to the kernel the rpmsg device tree to enable communication between the A53 cluster and the M7 one: u-boot=>setenv fdtfile imx8mp-evk-rpmsg.dtb u-boot=>saveenv Load the M7 example: u-boot=>setenv mmcargs 'setenv bootargs ${jh_clk} console=${console} root=${mmcroot} snd_pcm.max_alloc_per_card=134217728' u-boot=>saveenv Now, we need to load the M4 with the demo. Refer to [1] for further information. If running the BSP on an SD card, make sure the example binary is listed on the boot partition as follows: fatls mmc 1:1 You shall see something similar to this:             imx8mp_m7_TCM_sai_low_power_audio.bin Open the serial terminal emulator for the M7. Out of the fourth ports listed when we plug the i.MX 8M Plus serial debug cable to the PC, the M7 is typically the last one listed.   All the serial ports available to the workstation when the i.MX 8M Plus serial cable is connected to it. NOTE: you may require to install addtitional COM drivers if you are running on Windows. I like doing the previous step so I can see the result of the next commands issued in U-boot to load the M7 image. fatload mmc 1:1 0x48000000 imx8mp_m7_TCM_sai_low_power_audio.bin; cp.b 0x48000000 0x7e0000 20000; bootaux 0x7e0000 Here is an screenshot that shows how the U-Boot's response should look: U-Boot response when loading the SAI low power audio example to the Cortex M7 That should have prompted the following message on the M7 terminal: M7-core is up!   Now, let’s move to user space! u-boot=> boot 7. Testing the example using a simple GStreamer pipeline   As soon as the O.S. finishes booting. We can see that M7 terminal prompts the following: M7 is now in STOP mode; waiting for some audio to beat the room! Confirm that the WM8960 is listed as audio card as follows: cat /proc/asound/cards             Listing avaialable audio cards. WM8960 should be present. Make note of the list. The wm8960 is listed a the third sound card. This is where I like to differ a bit from [2] and I suggest a quicker test in case of not having an audio file ready. We just simply use GStreamer to play an audiotest source. Please make sure to plug in your headphones onto the board’s 3.5 mm jack before.   The following GStreamer pipeline is using the WM8960 as an audiosink.  gst-launch-1.0 audiotestsrc ! alsasink device=hw:3   NOTE: please be cautious and not put the headphones directly in your head at the first attempt. The sound can be too loud to some people. This is what you should see on the M7 side: Stop the GStreamer pipeline issuing CTRL + C. M7 shall warn you about that: NOTE: you can use the aplay command to play audio as shown on [2]. However, I consider using a testsrc is much quicker and flexible for a quick test.  8. Additional information   Feel free to go ahead and tweak the GStreamer pipeline to change audio test source properties. audiotest src. This command will let you know the available options:            gst-inspect-1.0 audiotestsrc                         NOTE: you can navigate through the displayed list using the “d”key. Press “q’’ to quit. For example:     For example, I am reproducing sound using a different setup based on the list above: gst-launch-1.0 audiotestsrc freq=4000 volume=0.8 wave=8 ! alsasink device=hw:3 9.  Errata and future updates   TBD:     Add an example on how to define the default audio card and play the audio either using gst-play or building the pipeline using filesrc Comment on the limitations of the M7 core regarding sample rate and audio formats  
View full article
This is based on L5.10.35 BSP where you have to install QT static build: Qt 5.15 static build: Assuming your sysroot is at "/sysroot-cross" and your toolchain is at "/Toolchain" your qt-source is at /Qt-5.15 PATH=/sysroot-cross/bin:/sysroot-cross/sbin:/Toolchain/bin mkdir /Qt-5.15/mkspecs/qws/linux-imx6-g++ create in this dir the textfile "qmake.conf" with this content: ####################### snip qmake.conf ############################## include(../../common/linux.conf) include(../../common/qws.conf) # modifications to g++.conf QMAKE_CC                = arm-linux-gnueabi-gcc QMAKE_CFLAGS            = -pipe -isystem /sysroot-cross/include -isystem /sysroot-cross/usr/include QMAKE_CXX               = arm-linux-gnueabi-g++ QMAKE_CXXFLAGS          = -pipe -isystem /sysroot-cross/include -isystem /sysroot-cross/usr/include QMAKE_INCDIR            = /sysroot-cross/include /sysroot-cross/usr/include QMAKE_LIBDIR            = /sysroot-cross/lib /sysroot-cross/usr/lib QMAKE_LINK              = arm-linux-gnueabi-g++ QMAKE_LINK_SHLIB        = arm-linux-gnueabi-g++ QMAKE_LFLAGS            = -L/sysroot-cross/lib -L/sysroot-cross/usr/lib -Wl,-rpath-link -Wl,/sysroot-cross/lib QMAKE_LFLAGS           += -Wl,-rpath-link -Wl,/sysroot-cross/usr/lib #Opengl QMAKE_INCDIR_OPENGL = /Vivante/include QMAKE_INCDIR_OPENGL += /Vivante/include/GL QMAKE_INCDIR_OPENGL += /Vivante/include/EGL QMAKE_INCDIR_OPENGL += /Vivante/include/GLES2 QMAKE_LIBDIR_OPENGL = /Vivante/lib QMAKE_INCDIR_OPENGL_ES1 = $$QMAKE_INCDIR_OPENGL QMAKE_LIBDIR_OPENGL_ES1 = $$QMAKE_LIBDIR_OPENGL QMAKE_INCDIR_OPENGL_ES1CL = $$QMAKE_INCDIR_OPENGL QMAKE_LIBDIR_OPENGL_ES1CL = $$QMAKE_LIBDIR_OPENGL QMAKE_INCDIR_OPENGL_ES2 = /Vivante/include QMAKE_INCDIR_OPENGL_ES2 += /Vivante/include/EGL QMAKE_INCDIR_OPENGL_ES2 += /Vivante/include/GLES2 QMAKE_LIBDIR_OPENGL_ES2 = $$QMAKE_LIBDIR_OPENGL QMAKE_INCDIR_EGL = $$QMAKE_INCDIR_OPENGL_ES2 QMAKE_LIBDIR_EGL = $$QMAKE_LIBDIR_OPENGL QMAKE_LIBS_EGL = -lEGL -lGAL -lGLESv2 -lGLES_CM QMAKE_LIBS_OPENGL_ES2 = -lEGL -lGAL -lGLESv2 -lGLES_CM QMAKE_LIBS_OPENGL = -lEGL -lGAL -lGLESv2 -lGLES_CM QMAKE_LIBS_OPENGL_QT = -lEGL -lGAL -lGLESv2 -lGLES_CM QMAKE_LIBS_OPENGL_ES1 = QMAKE_LIBS_OPENGL_ES1CL = # modifications to linux.conf QMAKE_AR                = arm-linux-gnueabi-ar cqs QMAKE_OBJCOPY           = arm-linux-gnueabi-objcopy QMAKE_STRIP             = arm-linux-gnueabi-strip QMAKE_CFLAGS_RELEASE   = -pipe -isystem /sysroot-cross/include -isystem /sysroot-cross/usr/include load(qt_config) ####################### snip qmake.conf ############################## create in the same dir the text file "qplatformdefs.h" ####################### snip qplatformdefs.h ############################## #include "../../linux-g++/qplatformdefs.h" ####################### snip qplatformdefs.h ############################## now goto dir /Qt-5.15 cd /Qt-5.15 call configure with ./configure -opensource -confirm-license -release -no-rpath -no-fast \     -no-sql-ibase -no-sql-mysql -no-sql-odbc -no-sql-psql -no-sql-sqlite2 \     -no-qt3support -no-mmx -no-3dnow -no-sse -no-sse2 -no-sse3 -no-ssse3 \     -no-sse4.1 -no-sse4.2 -no-avx -no-optimized-qmake -no-nis -no-cups -pch \     -reduce-relocations -force-pkg-config -prefix /usr -no-armfpa -make libs \     -nomake docs -little-endian -embedded armv6 -qt-decoration-styled \     -depths all -xplatform qws/linux-imx6-g++ -iconv -largefile -qt-gfx-linuxfb \     -qt-gfx-multiscreen -qt-mouse-pc -qt-mouse-linuxinput -qt-libpng \     -plugin-gfx-directfb -system-zlib -no-accessibility -no-gfx-transformed \     -no-gfx-qvfb -no-gfx-vnc -no-kbd-tty -no-kbd-linuxinput -no-kbd-qvfb \     -no-mouse-linuxtp -no-mouse-tslib -no-mouse-qvfb -no-libmng -no-libtiff \     -no-gif -no-libjpeg -no-freetype -no-stl -no-glib -no-openssl -no-egl \     -no-xmlpatterns -no-exceptions -no-multimedia -no-audio-backend -no-phonon \     -no-phonon-backend -no-webkit -no-script -no-scripttools -no-svg -no-script \     -no-declarative -no-sql-sqlite -no-qdbus -no-opengl -static -nomake tools \     -nomake examples -nomake demos when configuring is finished call make after a looong time, when everything goes right, we have a staticly compiled Qt. DO NOT call "make install". We will install manually: copy from /Qt-5.15/bin the files moc, uic, rcc and qmake to somewhere in PATH, eg. /sysroot-cross/bin copy the contents of dir /Qt-5.15/mkspecs to /sysroot-cross/usr/mkspec copy the contents of dir /Qt-5.15/plugins to /sysroot-cross/usr/plugins copy the contents of dir /Qt-5.15/include to /sysroot-cross/usr/include copy the contents of dir /Qt-5.15/lib to /sysroot-cross/usr/lib Test application camtest: if you don't have/want directfb plugin remove from camtest.pro the lines LIBS += -L/sysroot-cross/usr/plugins/gfxdrivers QTPLUGIN += QDirectFBScreen and the lines from main.cpp #include <QtPlugin> Q_IMPORT_PLUGIN(qdirectfbscreen) generate makefile by typing /sysroot-cross/bin/qmake -spec /sysroot-cross/usr/mkspecs/qws/linux-imx6-g++ camtest.pro then make you should set and activate your framebuffers with this script ################# snip ################################ fbset -fb /dev/fb0 -g 1024 768 1024 2304 16 echo -n 0 > /sys/class/graphics/fb0/blank fbset -fb /dev/fb1 -g 1024 768 1024 1536 32 echo -n 0 > /sys/class/graphics/fb1/blank modprobe galcore modprobe uvcvideo modprobe mxc_v4l2_capture ################# snip ################################ if you use directfb then your /etc/directfbrc file should look like this: ######################## snip /etc/directfbrc ############# system=fbdev fbdev=/dev/fb1 mode=1024x768 depth=32 pixelformat=ARGB no-cursor window-surface-policy=systemonly ######################## snip /etc/directfbrc ############# to start the application with directfb: ./camtest -qws -display directfb without directfb using linuxfb: ./camtest -qws -display linuxfb:/dev/fb1 Notes about application: 1. The application shows 2 webcams in background-framebuffer (BG-FB). The foreground-framebuffer (FG-FB) shows the qt-gui. FG-FB is configured to be fully opaque and uses color-keying. On the BG-FB one cam is overlayed on the other cam using IPU. Optimization possibilities: the app copies the frames from the cams with memcpy. This wouldn't be necessary, when the kernel usb-webcam interface (uvc) would support V4L2_MEMORY_USERPTR method. through this way, you could pass the mapped IPU mmapped inbufs directly to v4l2 output buffers. If you get errors like NOSPC (-28) from uvc, this is a limitation of USB. My board is a MX6QSabre, where the two webcams are connected to the same usb-controller. With both webcams I had to limit the frame size to 320x250 and 160x120 at 25Hz. You might try higher res if you have other type of webcams (not usb). Have fun  
View full article
This note show how to use the open source gstreamer1.0-rtsp-server package on i.MX6QDS and i.MX8x to stream video files and camera using RTP protocol.  The i.MX 6ULL and i.MX 7 doesn't have Video Processing Unit (VPU). Real Time protocol is a very common network protocol for delivering media over IP networks. On the board, you will need a GStreamer pipeline that encodes the raw video, adds the RTP payload, and sends over a network sink. A generic pipeline would look as follows: video source ! video encoder ! RTP payload ! network sink Video source: often it is a camera, but it can be a video from a file or a test pattern, for example. Video encoder: a video encoder as H.264, H.265, VP8, JPEG and others. RTP payload: an RTP payload that matches the video encoder. Network sink: a video sync that streams over the network, often via UDP.   Prerequisites: MX6x o MX8x board with the L5.10.35 BSP installed. A host PC with either Gstreamer or VLC player installed. Receiving h.264/h.265 Encoded RTP Video Stream on a Host Machine Using GStreamer GStreamer is a low-latency method for receiving RTP video. On your host machine, install Gstreamer and send the following command: $ gst-launch-1.0 -v udpsrc port=5000 caps = "application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, payload=(int)96" ! rtph264depay ! decodebin ! videoconvert ! autovideosink sync=false   Using Host PC: VLC Player Optionally, you can use VLC player to receive RTP video on a PC. First, in your PC, create a sdp file with the following content:  stream.sdpv=0m=video 5000 RTP/AVP 96c=IN IP4 127.0.0.1a=rtpmap:96 H264/90000 After this, with the GStreamer pipepline on the device running, open this .sdp file with VLC Player on the host PC. Sending h.264 and h.265 Encoded RTP Video Stream GStreamer provides an h.264 encoding element by software named x264enc. Use this plugin if your board does not support h.264 encoding by hardware or if you want to use the same pipeline on different modules. Note that the video performance will be lower compared with the plugins with encoding accelerated by hardware. # gst-launch-1.0 videotestsrc ! videoconvert ! x264enc ! rtph264pay config-interval=1 pt=96 ! udpsink host=<host-machine-ip> port=5000 Note: Replace <host-machine-ip> by the IP of the host machine. In all examples you can replace videotestsrc by v4l2src element to collect a stream from a camera   i.MX8X # gst-launch-1.0 videotestsrc ! videoconvert ! v4l2h264enc ! rtph264pay config-interval=1 pt=96 ! udpsink host=<host-machine-ip> port=5000   i.MX 8M Mini Quad/ 8M Plus # gst-launch-1.0 videotestsrc ! videoconvert ! vpuenc_h264 ! rtph264pay config-interval=1 pt=96 ! udpsink host=<host-machine-ip> port=5000 i.MX6X The i.MX6QDS does not support h.265 so the h.264 can work: # gst-launch-1.0 videotestsrc ! videoconvert ! vpuenc_h264 ! rtph264pay config-interval=1 pt=96 ! udpsink host=<host-machine-ip> port=5000   Using Other Video Encoders While examples of streaming video with other encoders are not provided, you may try it yourself. Use the gst-inspect tool to find available encoders and RTP payloaders on the board: # gst-inspect-1.0 | grep -e "encoder"# gst-inspect-1.0 | grep -e "rtp" -e " payloader" Then browse the results and replace the elements in the original pipelines. On the receiving end, you will have to use a corresponding payload. Inspect the payloader element to find the corresponding values. For example: # gst-inspect-1.0 rtph264pay   Install rtp in your yocto different form L5.10.35 BSP, to install gstreamer1.0-rtsp-server in any Yocto Project image, please follow the steps below: Enable meta-multimedia layer: Add the following on your build/conf/bblayers.conf: BBLAYERS += "$"${BSPDIR}/sources/meta-openembedded/meta-multimedia" Include gstreamer1.0-rtsp-server into the image: Add the following on your build/conf/local.conf: IMAGE_INSTALL_append += "gstreamer1.0-rtsp-server" Run bitbake and mount your sdcard. Copy the binaries: Access the gstreamer1.0-rtsp-server examples folder: $ cd /build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer1.0-rtsp-server/$version/build/examples/.libs Copy the test-uri and test-launch to the rootfs /usr/bin folder. $ sudo cp test-uri test-launch /media/USER/ROOTFS_PATH/usr/bin Be sure that the IPs are correctly set: SERVER: => ifconfig eth0 $SERVERIP CLIENT: => ifconfig eth0 $CLIENTIP Video file example SERVER: => test-uri file:///home/root/video_file.mp4 CLIENT: => gst-launch-1.0 playbin uri=rtsp://$SERVERIP:8554/test You can try to improve the framerate performance using manual pipelines in the CLIENT with the rtspsrc plugin instead of playbin. Follow an example: => gst-launch-1.0 rtspsrc location=rtsp://$SERVERIP:8554/test caps = 'application/x-rtp'  ! queue max-size-buffers=0 ! rtpjitterbuffer latency=100 ! queue max-size-buffers=0 ! rtph264depay ! queue max-size-buffers=0 ! decodebin ! queue max-size-buffers=0 ! imxv4l2sink sync=false   Camera example SERVER: => test-launch "( imxv4l2src device=/dev/video0 ! capsfilter caps='video/x-raw, width=1280, height=720, framerate=30/1, mapping=/test' ! vpuenc_h264 ! rtph264pay name=pay0 pt=96 )" CLIENT: => gst-launch-1.0 rtspsrc location=rtsp://$SERVERIP:8554/test ! decodebin ! autovideosink sync=false The rtspsrc has two properties very useful for RTSP streaming: Latency: Useful for low-latency RTSP stream playback (default 200 ms); Buffer-mode: Used to control buffer mode. The slave mode is recommended for low-latency communications. Using these properties, the example below gets 29 FPS without a sync=false property in the sink plugin. The key achievement here is the fact that there is no dropped frame: => gst-launch-1.0 rtspsrc location=rtsp://$SERVERIP:8554/test latency=100 buffer-mode=slave ! queue max-size-buffers=0 ! rtph264depay ! vpudec ! imxv4l2sink      
View full article
In order to get USB cameras (web cams) working on i.MX 51 EVK board running Ubuntu, a few steps must be followed, and they are: Enable USB Camera's drivers on Kernel Test it using Gstreamer or another compatible software (as Cheese) Kernel Driver USB cameras (web cameras) on Linux work over GSPCA driver, to enable this driver you need to go to: ./ltib -c   [*] Configure the kernel     Device Drivers -->          Multimedia Devices -->               [*] Video Capture Adapters -->                    [*] V4L USB Devices -->                         <*> USB Video Class (UVC)                                      [*] UVC input events device support                         <*> GSPCA Based WebCams --> From this point, you need to choose your specific driver. If you don't know, you can select all of those options as a built-in module "<*>" that will work. GSPCA Drivers USB Camera Detection Connect your USB camera to the USB Host port on i.MX 51 EVK board and then type "dmesg", and also check if there is a video0 device using: ubuntu@ubuntu-desktop:~$ ls /dev/video0 /dev/video0 USB Camera Detection Gstreamer Command Line In order to test your USB camera using Gstreamer plugin, use the following command line to perform it: ubuntu@ubuntu-desktop:~$ gst-launch-0.10 v4l2src ! ffmpegcolorspace ! ximagesink and the results: Hi there !!! EOF !
View full article
meta-avs-demos Yocto layer meta-avs-demos is a Yocto meta layer (complementary to the NXP BSP release for i.MX) published on CodeAurora that includes the additional required packages to support  Amazon's Alexa Voice Services SDK (AVS_SDK) applications. The build procedure is the described on the README.md of the corresponding branch. We have 2 fuctional branches now: imx-alexa-sdk: Support for Morty based i.mx releases imx7d-pico-avs-sdk_4.1.15-1.0.0: legacy support for Jethro releases The master branch is only used to collect manifest files, that used with repo init/sync commands will fetch the whole environment for the 2 special supported boards: i.MX7D Pico Pi and i.MX8M EVK. However the meta-avs-demos can be used with any i.MX board either. Recipes to include Amazon's Alexa Voice Services in your applications. The meta-avs-demos provides the required recipes to build an i.MX image with the support for running Alexa SDK. The imx-alexa-sdk branch is based on Morty and kernel 4.9.X and it supports the next builds: i.MX7D Pico Pi i.MX8M EVK Generic i.MX board For the i.MX7D Pico Pi and i.MX8M EVK there is an extended support for additional (external) Sound Cards like: TechNexion VoiceHat: 2Mic Array board with DSPConcepts SW support Synaptics Card: 2 Mic with Sensory WakeWord support The Generic i.MX is for any other regular i.MX board supported on the official NXP BSP releases. Only the default soundcard (embedded) on the board is supported. Sensory wakeword is currently only enabled for those with ARMV7 architecture. To support any external board like the VoiceHat or Synaptics is up to the user to include the additional patches/changes required. Build Instructions Follow the corresponding README file to follow the steps to build an image with Alexa SDK support README-IMX7D-PICOPI.md README-IMX8M-EVK.md README-IMX-GENERIC.md
View full article
Notes: + Run the pipelines in the presented order + The above example streams H263 video. + the gl command is equal to 'gst-launch' (two instead of 'gst-launch'.size() chars ) + Pending work: H264 test cases and other scenarios. Scenario Shell variables and pipelines # Export always these variables on the i.MX export VSALPHA=1 export WIDTH=320 export HEIGHT=240 export SEP=20 # decoded and displayed Uni-directional: from PC to i.MX. PC is streaming 4 H.263 streams and i.MX displays all in the screen. # On i.MX (Target) gl udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=8890 ! rtph263depay ! vpudec ! mfw_isink sync=false axis-top=0 axis-left=0 disp-width=$WIDTH disp-height=$HEIGHT & gl udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=8891 ! rtph263depay ! vpudec ! mfw_isink sync=false axis-top=0 axis-left=`expr $WIDTH + $SEP` disp-width=$WIDTH disp-height=$HEIGHT & gl udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=8892 ! rtph263depay ! vpudec ! mfw_isink sync=false axis-top=`expr $HEIGHT + $SEP` axis-left=0   disp-width=$WIDTH disp-height=$HEIGHT & gl udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=8893 ! rtph263depay ! vpudec ! mfw_isink sync=false axis-top=`expr $HEIGHT + $SEP` axis-left=`expr $WIDTH + $SEP` disp-width=$WIDTH disp-height=$HEIGHT & # On PC (Source) export IP_iMX= # Place the IP address of the i.MX board gst-launch -v videotestsrc ! ffenc_h263 ! rtph263pay ! multiudpsink clients=IP_iMX:8890,IP_iMX:8891,IP_iMX:8892,$IP_iMX:8893 Uni-directional: from PC to i.MX. PC is streaming one H.264 stream and i.MX displays it on the screen # On i.MX (Target) # Make sure you set the caps correctly, specially the sprop-parameter-sets cap. The one show below is just an example and works with the source file sintel_trailer-1080p.mp4 export VSALPHA=1 GST_DEBUG=*:2 gst-launch -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, sprop-parameter-sets=(string)\"Z2QAMqw05gHgCJ+WEAAAAwAQAAADAwDxgxmg\\,aOl4TLIs\", payload=(int)96' port=8890 ! rtph264depay ! vpudec ! mfw_isink sync=false # On PC (Source) gst-launch -v filesrc location=sintel_trailer-1080p.mp4 typefind=true ! qtdemux ! rtph264pay ! multiudpsink clients=10.112.102.168:8890 Bi-directional: PC is streaming 4 H.263 streams to i.MX, iMX displays it and sends the four back to PC # On i.MX export IP_PC= # Place the IP address of the PC host machine gl -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=8890 ! rtph263depay ! vpudec ! tee name=t ! queue ! mfw_isink sync=false axis-top=0 axis-left=0 disp-width=$WIDTH disp-height=$HEIGHT t. ! queue ! vpuenc codec=5 ! rtph263pay ! udpsink host=$IP_PC port=9990 & gl -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=8891 ! rtph263depay ! vpudec ! tee name=t ! queue ! mfw_isink sync=false axis-top=0 axis-left=`expr $WIDTH + $SEP` disp-width=$WIDTH disp-height=$HEIGHT t. ! queue ! vpuenc codec=5 ! rtph263pay ! udpsink host=$IP_PC port=9991 & gl -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=8892 ! rtph263depay ! vpudec ! tee name=t ! queue ! mfw_isink sync=false axis-top=`expr $HEIGHT + $SEP` axis-left=0   disp-width=$WIDTH disp-height=$HEIGHT t. ! queue ! vpuenc codec=5 ! rtph263pay ! udpsink host=$IP_PC port=9992 & gl -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=8893 ! rtph263depay ! vpudec ! tee name=t ! queue ! mfw_isink sync=false axis-top=`expr $HEIGHT + $SEP` axis-left=`expr $WIDTH + $SEP` disp-width=$WIDTH disp-height=$HEIGHT t. ! queue ! vpuenc codec=5 ! rtph263pay ! udpsink host=$IP_PC port=9993 & # On PC ## Stream received from iMX export IP_iMX= # Place the IP address of the i.MX board gl -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=9990 ! rtph263depay ! ffdec_h263 ! xvimagesink & gl -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=9991 ! rtph263depay ! ffdec_h263 ! xvimagesink & gl -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=9992 ! rtph263depay ! ffdec_h263 ! xvimagesink & gl -v udpsrc caps='application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H263' port=9993 ! rtph263depay ! ffdec_h263 ! xvimagesink & ## Stream sent to iMX gl -v videotestsrc ! videoscale ! video/x-raw-yuv,width=\(int\)1408,height=\(int\)1152 !  ffenc_h263 ! rtph263pay ! udpsink host=$IP_iMX port=8890 & gl -v videotestsrc ! videoscale ! video/x-raw-yuv,width=\(int\)1408,height=\(int\)1152 ! ffenc_h263 ! rtph263pay ! udpsink host=$IP_iMX port=8891 & gl -v videotestsrc ! videoscale ! video/x-raw-yuv,width=\(int\)1408,height=\(int\)1152 ! ffenc_h263 ! rtph263pay ! udpsink host=$IP_iMX port=8892 & gl -v videotestsrc ! videoscale ! video/x-raw-yuv,width=\(int\)1408,height=\(int\)1152 ! ffenc_h263 ! rtph263pay ! udpsink host=$IP_iMX port=8893 &
View full article
GStreamer has a simple feature to enable tracing, allowing the developer to do basic debugging. These can be done in two ways: Adding the parameter --gst-debug=LIST to the pipeline (a pipeline is a executed gst-launch command) Prepending the environment variable GST_DEBUG=LIST' LIST is a a comma-separated argument, indicating the GStreamer elements to trace. For example, if one needs to trace the sink element      $ GST_DEBUG=*sink*:5 gst-launch playbin2 uri=file:///sample.avi or      $ gst-launch playbin2 uri=file:///sample.avi --gst-debug=*sink*:5 Both commands produces the same log. In case want to trace for than one element, so can simple add the <element>:5, for example      $ GST_DEBUG=mfw_v4lsink:5,vpudec:5 gst-launch playbin2 uri=file:///sample.avi The number 5 indicates the log category, where 5 is the highest (the most verbose log you can get) and 0 produces no output (5=LOG, 4=DEBUG, 3=INFO, 2=WARN, 1=ERROR). Log can be huge in each pipeline run. One way to filter it is using the grep command. Before grepping, one needs to redirect the standard error to the standard output (GStreamer log goes always to stderr), so      $ GST_DEBUG=mfw_v4lsink:5,vpudec:5 gst-launch playbin2 uri=file:///sample.avi 2>&1 | grep <filter string> In case the log needs to be shared, it is important to remove the 'color' of the log, again, one just needs to add the parameter --gst-debug-no-color or prepend the env variable GST_DEBUG_NO_COLOR=1 ----- More shell variables that GStreamer react, can be found here https://developer.gnome.org/gstreamer/0.10/gst-running.html
View full article
gst-inspect is a tool to to get documentation about GStreamer elements. Pipeline Check installed GST elements gst-inspect | tail -1 Check installed FSL GST elements gst-inspect | grep imx Element documentation gst-inspect <gst element>
View full article
Recently I published this i.MX Dev Blog post about the Gateworks plugin gst-variable-rtsp-server support for i.MX 6. Now, you can check how to use it on i.MX 8 SoCs as well. 1. Preparing the image In order to use gst-variable-rtsp-server plugin, prepare your machine and distro: Add the following line to conf/local.conf: IMAGE_INSTALL_append += "gstreamer1.0-rtsp-server gst-variable-rtsp-server" Download the attached patch and apply it by doing: $ cd <yocto_path>/sources/meta-fsl-bsp-release/ $ git am ~/Download/0001-Add-RTSP-support-for-i.MX-8-L4.14.78_ga1.0.0-or-olde.patch Note: This patch is not necessary for L4.14.98_ga2.0.0 BSP! Then, build the image with bitbake and deploy it to the SD card. 2. Video Test Source Example Server $ gst-variable-rtsp-server -p 9001 -u "videotestsrc ! v4l2h264enc ! rtph264pay name=pay0 pt=96" Client 2. Camera Example Server $ gst-variable-rtsp-server -p 9001 -u "v4l2src device=/dev/video0 ! video/x-raw,width=640,height=480 ! v4l2h264enc ! rtph264pay name=pay0 pt=96" Client In order to use VLC or other application as the client, just enter the URL as shown in the image below:
View full article
This document describes the i.MX 8MQ EVK HDMI output and mini-SAS connectors features on Linux and Android use cases, covering the supported daughter-board, the process to change Device Tree (DTS) files or Boot Images, and enable these different display options on the board.
View full article
Qt framework Qt is a cross-platform complete development framework with tools designed to streamline the creation of stunning native applications and amazing user interfaces for desktop, embedded and mobile platforms. Qt's cross-platform full framework and tools enables developers to target various desktop, embedded, mobile and real-time operating systems with one code base. Qt brings freedom to the developer saving development time, adding efficiency and ultimately shortening time to market. Building Qt Compile Qt for i.MX28 Building QT5 for i.MX53 Building QT for i.MX6 Qt on iMX6 Installing tools Installing and Configuring QT Creator (Ubuntu) Qt5 with Qt3D over Wayland rootfs Demos Qt5 Cinematic Experience Demo on i.MX6 Video - IMx 53 Qt5 qt3d demo Qt5 with Qt3D over Wayland rootfs Information Qt5 on i.MX6  DO's and DONT's Best Practices for QML
View full article
Description       this doc is explain how to develop a audio card driver base on i.MX6 platform. which explain the ASOC architecture struction basic knowledage and then give some sample for the audio driver development like: 1:NXP SGTL5000: NXP i.MX BSP sabrelite board default support it. 2: Wolfson WM8524.    A: 3.0.35 BSP support: i.MX6 setbox BSP support it:(which in elder fsl community link and out of data)    B: 3.14.28 BSP support pls check attachment: 3: Wolfson WM8960.     which include how to add the android middle-layer and driver, pls check attachment. 4: TI TLV320AIC3120      which include how to add the android middle-layer and driver, pls check attachment. 5: TI TLV320AIC3X   Products Product Category NXP Part Number URL MPU i.MX6 Family https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-processors/i-mx-6-processors:IMX6X_SERIES   Tools NXP Development Board URL i.MX6 SabreSDP https://www.nxp.com/design/development-boards:EVDEBRDSSYS#/collection=softwaretools&start=0&max=25&query=typeTax%3E%3Et633::archived%3E%3E0::Sub_Asset_Type%3E%3ETSP::deviceTax%3E%3Ec731_c380_c127_c126&sorting=Buy%2FSpecifications.desc&language=en&siblings=false which have a doc MX6X_ASOC_V5-20191115.pdf and related driver sample codes.
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343528 
View full article
///////////////////////////create device node /dev/galcore///////////////////////////// $home/myandroid/kernel_imx/drivers/mxc/gpu-viv/Kbuild MODULE_NAME ?= galcore /* define node name*/ $home/myandroid/kernel_imx/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_linux.h define DEVICE_NAME "galcore" $home/myandroid/kernel_imx/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_probe.c drv_init call ret = register_chrdev(major, DEVICE_NAME, &driver_fops); ///////////////////////////////opengles2 functios/////////////////////////////////////////// myandroid/device/fsl-proprietary/gpu-viv/lib/egl/libGLESv2_VIVANTE.so glActiveTexture glBindBuffer ... ... ... //those glxxxxxx call into sub_D40C int __fastcall sub_D40C(int a1, int a2, int a3) //address 0x0000D40C { int result; // r0@1 int v4; int v5; v4 = a2;   v5 = a3;   gcoOS_GetTLS(&v4);  //------------> goto libGAL.so   result = v4;   if ( v4 )     result = *(_DWORD *)(v4 + 36);   return result; } and $home/myandroid/device/fsl-proprietary/gpu-viv/lib/libGAL.so //export function signed int __fastcall gcoOS_GetTLS(void **a1) { ... ... gcoOS_GetTLS v4 = open("/dev/galcore", 2); ... ... } and device node /dev/galcore pass command into module galcore $home/myandroid/kernel_imx/drivers/mxc/gpu-viv/hal/kernel/gc_hal_kernel.c gckKERNEL_Dispatch This document was generated from the following discussion: Share Vivante 3d gc2000 work flow
View full article
MIPI can support video streaming over 1, 2, 3 and 4 lanes. On i.MX6 Sabre boards, the OV5640 camera supports 1 or 2 lanes and the NXP Linux Kernel uses 2 lanes as default. In order to use only one lane, follow the steps below: 1 - Change the board Device Tree on Linux Kernel. On file <linux kernel folder>/arch/arm/boot/dts/imx6qdl-sabresd.dtsi, find the entry "&mipi_csi" and change lanes from 2 to 1. 2 - Configure OV5640 to use only one lane instead of two. On file <linux kernel folder>/drivers/media/platform/mxc/capture/ov5640_mipi.c, change the register 0x300e value from 0x45 to 0x05. This register setup is located at struct ov5640_init_setting_30fps_VGA. 3 - Build the kernel and device tree files. 4 - Test the camera. Unit test can be used to test the video capture: /unit_tests/mxc_v4l2_overlay.out -di /dev/video1 -ow 1024 -oh 768 -m 1 5 - Checking if it's really using one lane. MIPI_CSI_PHY_STATE resgister (address 0x021D_C014) provides the status of all data and clock lanes. During video streaming using 2 lanes, the register value constantly changes its value between 0x0000_0300 and 0x0000_0330. When using only one lane, this register value constantly changes its value between 0x0000_0300 and 0x0000_0310. To read the register value during the stream, run the video test with &: /unit_tests/mxc_v4l2_overlay.out -di /dev/video1 -ow 1024 -oh 768 -m 1 & Now, run the memtool: /unit_tests/memtool -32 0x021dc014 1 i.MX6DL running mxc_v4l2_overlay.out with only one lane:
View full article
All Boards Creating App MP3 OpenEmbedded
View full article
When streaming, if you want to play a streaming URL, it can be inconvenient if the browser cannot recognize the URL as a media stream and downloads the content rather than using Gallery to play it. To create this kind of media streaming, you need to write an apk to use VideoView to play the URL/media stream from the console. Here is the command of how to play a media file or network stream from console. Gingerbread am start -n com.cooliris.media/com.cooliris.media.MovieView -d "<URL>"       The URL can be file position or network stream URL, such as: you can play a local file by: am start -n com.cooliris.media/com.cooliris.media.MovieView -d "/mnt/sdcard/test.mp4" You can also play a http stream by: am start -n com.cooliris.media/com.cooliris.media.MovieView -d "http://v.iask.com/v_play_ipad.php?vid=76710932" Or play a rtsp stream by: am start -n com.cooliris.media/com.cooliris.media.MovieView -d "rtsp://10.0.2.1:554/stream" ICS am start -n com.android.gallery3d/com.android.gallery3d.app.MovieActivity -d "<URL>"        The URL has the same definition of Gingerbread.
View full article
This PDF is training material for showing examples on video encoding, video decoding, video streaming on an i.MX53QSB board.
View full article