i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
This is a quick article focused on how to add the support of the ssh on the i.MX devices using Yocto to add that packages.   Refer to the pdf attached.
查看全文
This document describes the steps to create your own out-of-tree kernel module recipe for Yocto.
查看全文
Symptoms   When configure a gpio pin for a driver in the dts/dtsi file like below example,   e.g.   a-switch {            compatible = "a-switch-driver";            pinctrl-names = "default";            pinctrl-0 = <&pinctrl_switch>;            gpios = <&lsio_gpio1 1 GPIO_ACTIVE_HIGH>;            status = "okay"; };   pinctrl_switch: switch_gpio {     fsl,pins = < IMX8QXP_SPI2_SDO_LSIO_GPIO1_IO01    0x21 >; };   then you may get the error when request the gpio in the driver during the kernel boot up.   Error message like this: a-switch: failed to request gpio a-switch: probe of a-switch failed with error -22   Linux version: L5.4.x   Diagnosis   Because the gpio_mxc_init function run before the function imx_scu_driver_init. The pm_domains for gpio is not ready before running mxc_gpio_probe, so gpio request will be failed.     Solution   There are two ways to resolve this issue 1. Build the driver as a module. i.e. select the driver in kernel’s menuconfig as “M”. Then , run “insmod” to load the driver after the kernel boot up.   OR   2. Apply below patch, let gpio driver init after scu driver. diff --git a/drivers/gpio/gpio-mxc.c b/drivers/gpio/gpio-mxc.c index 1dfe513f8fcf..52b5799040b3 100644 --- a/drivers/gpio/gpio-mxc.c +++ b/drivers/gpio/gpio-mxc.c @@ -892,7 +892,7 @@ static int __init gpio_mxc_init(void) return platform_driver_register(&mxc_gpio_driver); } -subsys_initcall(gpio_mxc_init); +device_initcall(gpio_mxc_init);  
查看全文
In some cases, i.MX board connect to different module. It has very tiny changes, such as just one gpio different driver strength. We can build an entire new software to handle this requirement. Here we introduce another way, using u-boot to modify the device tree(dtb) at runtime.   Here is u-boot fdt command for  How to use gpio-hog demo https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-use-gpio-hog-demo/ta-p/1317709   run loadfdt fdt addr ${fdt_addr_r} fdt print /soc/bus/pinctrl/uart3grp fdt rm /soc/bus/pinctrl/uart3grp fdt print serial2 fdt set serial2 status disabled fdt print serial2 fdt print gpio4 fdt resize fdt mknode gpio4 gpio_hog_demo fdt set gpio4/gpio_hog_demo gpio-hog fdt set gpio4/gpio_hog_demo gpios <7 0> fdt set gpio4/gpio_hog_demo output-high fdt print gpio4 run mmcargs run loadimage booti ${loadaddr} - ${fdt_addr_r} root@imx8mmevk:~# cat /sys/kernel/debug/gpio gpiochip0: GPIOs 0-31, parent: platform/30200000.gpio, 30200000.gpio: gpio-5 ( |PCIe DIS ) out hi gpio-13 ( |ir-receiver ) in hi IRQ ACTIVE LOW gpio-15 ( |cd ) in hi IRQ ACTIVE LOW gpiochip1: GPIOs 32-63, parent: platform/30210000.gpio, 30210000.gpio: gpio-38 ( |? ) out hi gpio-42 ( |reset ) out lo ACTIVE LOW gpio-51 ( |regulator-usdhc2 ) out lo gpiochip2: GPIOs 64-95, parent: platform/30220000.gpio, 30220000.gpio: gpio-80 ( |status ) out hi gpiochip3: GPIOs 96-127, parent: platform/30230000.gpio, 30230000.gpio: gpio-117 ( |PCIe reset ) out hi gpiochip4: GPIOs 128-159, parent: platform/30240000.gpio, 30240000.gpio: gpio-135 ( |gpio_hog_demo ) out hi gpio-141 ( |spi1 CS0 ) out hi ACTIVE LOW gpio-149 ( |wlf,mute ) out hi ACTIVE LOW root@imx8mmevk:~# [ 33.758914] VSD_3V3: disabling dtc_utils-v1.6.1-win-x86_64.zip by msys2   
查看全文
Application Note AN13872  Enabling SWUpdate on i.MX 6ULL, i.MX 8M Mini, and i.MX 93 is available on www.nxp.com    SWUpdate: Embedded Systems become more and more complex. Software for Embedded Systems have new features and fixes can be updated in a reliable way. Most of time, we need OTA(Over-The-Air) to upgrade the system. Like Android has its own update system. Linux also need an update system. SWUpdate project is thought to help to update an embedded system from a storage media or from network. However, it should be mainly considered as a framework, where further protocols or installers (in SWUpdate they are called handlers) can be easily added to the application. Mongoose daemon mode: Mongoose is a daemon mode of SWUpdate that provides a web server, web interface and web application. Mongoose is running on the target board(i.MX8MM EVK/i.MX8QXP MEK).Using Web browser to access it.   Suricatta daemon mode: Suricatta regularly polls a remote server for updates, downloads, and installs them. Thereafter, it reboots the system and reports the update status to the server. The screenshot is SWUpdate scuricatta working with hawkbit server.          
查看全文
adv7180 is the 8 bits parallel CSI interface TVin to iMX8QXP validation board. Its weaving mode de-interlace can be supported on both iMX8QXP B0 and C0 chips, but blending mode de-interlace can only work on iMX8QXP C0 chips.   ISL79987 is the 4 virtual channel TVin chip which can input 4 CVBS cameras to iMX8QXP with MIPI CSI2 inteface, it can only work with iMX8QXP C0 chips. The iMX8QXP B0 chips have MIPI CSI2 virtual channel errata.   To test the capture to file: $ /unit_tests/V4L2/mx8_v4l2_cap_drm.out -cam 1 -num 300 -fmt YUYV -of   To test the preview on screen: $ killall weston $ /unit_tests/V4L2/mx8_v4l2_cap_drm.out -cam 1 -fmt RGBP -num 30000   Note: 1. For weaving mode de-interlace, when the ISI is doing de-interlace, it can't do CSC at the same time, so preview will get color issue, because the real output video is always YUYV format. 2. For blending mode de-interlace, it must use ISI0, so for ISL79987, only one camera can use blending mode, the other three cameras are still using weaving mode. The preview color is OK for such use case. 3. The patch is for L4.19.35 BSP.     2019-11-14 update: Add the test application "mx8_v4l2_cap_drm.tar.gz" to support YUYV render to display. Test command to render 4 weaving mode cameras:    ./mx8_v4l2_cap_drm.out -cam 0xF -fmt YUYV -num 30000     2020-04-29 update: Add "0006-isl7998x-fix-the-mipi_bps-overwrite-issue-from-set_f.patch", it fixed the issue that MIPI bps information in isl7998x_data->format.reserved[0] had been overwritten by isl7998x_set_fmt().   2021-06-11 update: Added the patches based on L5.4.70_2.3.0 GA BSP.
查看全文
    Xenomai is real-time framework, which can run seamlessly side-by-side Linux as a co-kernel system, or natively over mainline Linux kernels (with or without PREEMPT-RT patch). The dual kernel nicknamed Cobalt, is a significant rework of the Xenomai 2.x system. Cobalt implements the RTDM specification for interfacing with real-time device drivers. The native linux version, an enhanced implementation of the experimental Xenomai/SOLO work, is called Mercury. In this environment, only a standalone implementation of the RTDM specification in a kernel module is required, for interfacing the RTDM-compliant device drivers with the native kernel. You can get more detailed information from Home · Wiki · xenomai / xenomai · GitLab       I have ported xenomai 3.1 to i.MX Yocto 4.19.35-1.1.0, and currently support ARM64 and test on i.MX8MQ EVK board. I did over night test( 5 real-time threads + GPU SDK test case) and stress test by tool stress-ng on i.MX8MQ EVK board. It looks lile pretty good. Current version (20200730) also support i.MX8MM EVK.     You need git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git, and git checkout xenomai-4.19.35-1.1.0-20200818 (which inlcudes all patches and bb file) and add the following variable in conf/local.conf before build xenomai by command bitbake xenomai.  XENOMAI_KERNEL_MODE = "cobalt"  PREFERRED_VERSION_linux-imx = "4.19-${XENOMAI_KERNEL_MODE}" IMAGE_INSTALL_append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" PREFERRED_VERSION_linux-imx = "4.19-${XENOMAI_KERNEL_MODE}" IMAGE_INSTALL_append += " xenomai" If XENOMAI_KERNEL_MODE = "cobalt", you can build dual kernel version. And If XENOMAI_KERNEL_MODE = "mercury", it is single kernel with PREEMPT-RT patch. The following is test result by the command (/usr/xenomai/demo/cyclictest -p 99 -t 5 -m -n -i 1000  -l 100000😞 //Over normal Linux kernel without GPU SDK test case T: 0 ( 4220) P:99 I:1000 C: 100000 Min: 7 Act: 10 Avg: 9 Max: 23 T: 1 ( 4221) P:99 I:1500 C: 66672 Min: 7 Act: 10 Avg: 10 Max: 20 T: 2 ( 4222) P:99 I:2000 C: 50001 Min: 7 Act: 12 Avg: 10 Max: 81 T: 3 ( 4223) P:99 I:2500 C: 39998 Min: 7 Act: 11 Avg: 10 Max: 29 T: 4 ( 4224) P:99 I:3000 C: 33330 Min: 7 Act: 13 Avg: 10 Max: 26 //Over normal Linux kernel with GPU SDK test case T: 0 ( 4177) P:99 I:1000 C: 100000 Min: 7 Act: 10 Avg: 11 Max: 51 T: 1 ( 4178) P:99 I:1500 C: 66673 Min: 7 Act: 12 Avg: 10 Max: 35 T: 2 ( 4179) P:99 I:2000 C: 50002 Min: 7 Act: 12 Avg: 11 Max: 38 T: 3 ( 4180) P:99 I:2500 C: 39999 Min: 7 Act: 12 Avg: 11 Max: 42 T: 4 ( 4181) P:99 I:3000 C: 33330 Min: 7 Act: 12 Avg: 11 Max: 36   //Cobalt with stress-ng --cpu 4 --io 2 --vm 1 --vm-bytes 512M --timeout 600s --metrics-brief T: 0 ( 4259) P:50 I:1000 C:3508590 Min:      0 Act:    0 Avg:    0 Max:      42 T: 1 ( 4260) P:50 I:1500 C:2338831 Min:      0 Act:    1 Avg:    0 Max:      36 T: 2 ( 4261) P:50 I:2000 C:1754123 Min:      0 Act:    1 Avg:    1 Max:      42 T: 3 ( 4262) P:50 I:2500 C:1403298 Min:      0 Act:    1 Avg:    1 Max:      45 T: 4 ( 4263) P:50 I:3000 C:1169415 Min:      0 Act:    1 Avg:    1 Max:      22   //Cobalt without GPU SDK test case T: 0 ( 4230) P:50 I:1000 C: 100000 Min: 0 Act: 0 Avg: 0 Max: 4 T: 1 ( 4231) P:50 I:1500 C:   66676 Min: 0 Act: 1 Avg: 0 Max: 4 T: 2 ( 4232) P:50 I:2000 C:   50007 Min: 0 Act: 1 Avg: 0 Max: 8 T: 3 ( 4233) P:50 I:2500 C:   40005 Min: 0 Act: 1 Avg: 0 Max: 3 T: 4 ( 4234) P:50 I:3000 C:   33338 Min: 0 Act: 1 Avg: 0 Max: 5 //Cobalt with GPU SDK test case T: 0 ( 4184) P:99 I:1000 C:37722968 Min: 0 Act: 1 Avg: 0 Max: 24 T: 1 ( 4185) P:99 I:1500 C:25148645 Min: 0 Act: 1 Avg: 0 Max: 33 T: 2 ( 4186) P:99 I:2000 C:18861483 Min: 0 Act: 1 Avg: 0 Max: 22 T: 3 ( 4187) P:99 I:2500 C:15089187 Min: 0 Act: 1 Avg: 0 Max: 23 T: 4 ( 4188) P:99 I:3000 C:12574322 Min: 0 Act: 1 Avg: 0 Max: 29 //Mercury without GPU SDK test case T: 0 ( 4287) P:99 I:1000 C:1000000 Min: 6 Act: 7 Avg: 7 Max: 20 T: 1 ( 4288) P:99 I:1500 C:  666667 Min: 6 Act: 9 Avg: 7 Max: 17 T: 2 ( 4289) P:99 I:2000 C:  499994 Min: 6 Act: 8 Avg: 7 Max: 24 T: 3 ( 4290) P:99 I:2500 C:  399991 Min: 6 Act: 9 Avg: 7 Max: 19 T: 4 ( 4291) P:99 I:3000 C:  333322 Min: 6 Act: 8 Avg: 7 Max: 21 //Mercury with GPU SDK test case T: 0 ( 4222) P:99 I:1000 C:1236790 Min: 6 Act: 7 Avg: 7 Max: 55 T: 1 ( 4223) P:99 I:1500 C:  824518 Min: 6 Act: 7 Avg: 7 Max: 44 T: 2 ( 4224) P:99 I:2000 C:  618382 Min: 6 Act: 8 Avg: 8 Max: 88 T: 3 ( 4225) P:99 I:2500 C:  494701 Min: 6 Act: 7 Avg: 8 Max: 49 T: 4 ( 4226) P:99 I:3000 C:  412247 Min: 6 Act: 7 Avg: 8 Max: 53 //////////////////////////////////////// Update for Yocto L5.4.47 2.2.0  /////////////////////////////////////////////////////////// New release for Yocto release L5.4.47 2.2.0 and it supports i.MX8M series (8MQ,8MM,8MN and 8MP). You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git,  and git checkout xenomai-5.4.47-2.2.0. You need to add the following variable in conf/local.conf before build xenomai by command bitbake imx-image-multimedia.  XENOMAI_KERNEL_MODE = "cobalt"  PREFERRED_VERSION_linux-imx = "5-${XENOMAI_KERNEL_MODE}" IMAGE_INSTALL_append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" PREFERRED_VERSION_linux-imx = "5-${XENOMAI_KERNEL_MODE}" IMAGE_INSTALL_append += " xenomai" //////////////////////////////////////// Update for Yocto L5.4.70 2.3.0  /////////////////////////////////////////////////////////// New release  for Yocto release L5.4.70 2.3.0 and it supports i.MX8M series (8MQ,8MM,8MN and 8MP) and i.MX8QM/QXP. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git and git checkout xenomai-5.4.70-2.3.0. Updating: 1, Support i.MX8QM and i.MX8QXP 2, Fix altency's the issue which uses legacy API to get time   //////////////////////////////////////// update for Yocto L5.4.70 2.3.2  /////////////////////////////////////////////////////////// New release for Yocto release L5.4.70 2.3.2. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git, and git checkout xenomai-5.4.70-2.3.2. Updating: 1, Enable Xenomai RTDM driver in Linux Kernel 2, Currently CAN, UART, GPIO,  SPI and Ethernet (in debug for RTNet)  are added in Xenomai. 3, Add KERNEL_DEVICETREE += " freescale/imx8mp-rt-evk.dtb " in sources/meta-imx/meta-bsp/conf/machine/imx8mpevk.conf to enable relative device in Xenomai domain, for example rt-imx8mp-flexcan.   //////////////////////////////////////// Update for Yocto L5.4.70 2.3.4  /////////////////////////////////////////////////////////// New release for Yocto release L5.4.70 2.3.4. You need to git clone  https://gitee.com/zxd2021-imx/xenomai-arm64.git and git checkout xenomai-5.4.70-2.3.4. Updating: 1, Enable RTNet FEC driver 2, Currently CAN, UART, GPIO,  SPI and Ethernet ( FEC Controller)  are added in Xenomai. 3, Add KERNEL_DEVICETREE += " freescale/imx8mp-rt-evk.dtb " in sources/meta-imx/meta-bsp/conf/machine/imx8mpevk.conf and KERNEL_DEVICETREE += " freescale/imx8mm-rt-ddr4-evk.dtb " in sources/meta-imx/meta-bsp/conf/machine/imx8mmddr4evk.conf to enable rt_fec device in Xenomai domain. Verifying the network connection by RTnet Ping Between i.MX8M Mini EVK and i.MX8M Plus EVK a, Setup test environment 1, Connect ENET1 of  i.MX8M Plus EVK (used as a master) and  ENET of i.MX8M Mini EVK (used as a slave) of  to a switch or hub 2, Modify /usr/xenomai/etc/rtnet.conf in i.MX8M Plus EVK board as the following: @@ -16,7 +16,7 @@ MODULE_EXT=".ko" # RT-NIC driver -RT_DRIVER="rt_eepro100" +RT_DRIVER="rt_fec" RT_DRIVER_OPTIONS="" # PCI addresses of RT-NICs to claim (format: 0000:00:00.0) @@ -30,8 +30,8 @@ REBIND_RT_NICS="" # The TDMA_CONFIG file overrides these parameters for masters and backup # masters. Leave blank if you do not use IP addresses or if this station is # intended to retrieve its IP from the master based on its MAC address. -IPADDR="10.0.0.1" -NETMASK="" +IPADDR="192.168.100.101" +NETMASK="255.255.255.0" # Start realtime loopback device ("yes" or "no") RT_LOOPBACK="yes" @@ -65,7 +65,7 @@ TDMA_MODE="master" # Master parameters # Simple setup: List of TDMA slaves -TDMA_SLAVES="10.0.0.2 10.0.0.3 10.0.0.4" +TDMA_SLAVES="192.168.100.102" # Simple setup: Cycle time in microsecond TDMA_CYCLE="5000" 3, Modify /usr/xenomai/etc/rtnet.conf in i.MX8M Mini EVK board as the following: @@ -16,7 +16,7 @@ MODULE_EXT=".ko" # RT-NIC driver -RT_DRIVER="rt_eepro100" +RT_DRIVER="rt_fec" RT_DRIVER_OPTIONS="" # PCI addresses of RT-NICs to claim (format: 0000:00:00.0) @@ -30,8 +30,8 @@ REBIND_RT_NICS="" # The TDMA_CONFIG file overrides these parameters for masters and backup # masters. Leave blank if you do not use IP addresses or if this station is # intended to retrieve its IP from the master based on its MAC address. -IPADDR="10.0.0.1" -NETMASK="" +IPADDR="192.168.100.102" +NETMASK="255.255.255.0" # Start realtime loopback device ("yes" or "no") RT_LOOPBACK="yes" @@ -59,13 +59,13 @@ STAGE_2_CMDS="" # TDMA mode of the station ("master" or "slave") # Start backup masters in slave mode, it will then be switched to master # mode automatically during startup. -TDMA_MODE="master" +TDMA_MODE="slave" # Master parameters # Simple setup: List of TDMA slaves -TDMA_SLAVES="10.0.0.2 10.0.0.3 10.0.0.4" +TDMA_SLAVES="192.168.100.102" # Simple setup: Cycle time in microsecond TDMA_CYCLE="5000" 4, rename imx8mm-rt-ddr4-evk.dtb to imx8mm-ddr4-evk.dtb in /run/media/mmcblk1p1,  rename imx8mp-rt-evk.dtb to imx8mp-evk.dtb in /run/media/mmcblk1p1, and reboot board. 5, Run the below command on i.MX8M Mini EVK board. cd /usr/xenomai/sbin/ ./rtnet start & 5, Run the below command on i.MX8M Plus EVK board. cd /usr/xenomai/sbin/ ./rtnet start & When you see the log (rt_fec_main 30be0000.ethernet (unnamed net_device) (uninitialized): Link is Up - 100Mbps/Full - flow control rx/tx) and you can run command "./rtroute" to check route table if the slave IP (192.168.100.102) is in route.. b, Verify the network connection using the command below: ./rtping -s 1024 192.168.100.102 //////////////////////////////////////// Update for Yocto L5.10.52 2.1.0  /////////////////////////////////////////////////////////// New release for Yocto release L5.10.52 2.1.0. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git and git checkout xenomai-5.10.52-2.1.0. Updating: 1, Upgrade Xenomai to v3.2 2, Enable Dovetail instead of ipipe. Copy xenomai-arm64 to <Yocto folder>/sources/meta-imx/meta-bsp/recipes-kernel, and add the following variable in conf/local.conf before build Image with xenomai enable by command bitbake imx-image-multimedia. XENOMAI_KERNEL_MODE = "cobalt" IMAGE_INSTALL_append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" IMAGE_INSTALL_append += " xenomai" Notice: If XENOMAI_KERNEL_MODE = "cobalt", you can build dual kernel version. And If XENOMAI_KERNEL_MODE = "mercury", it is single kernel with PREEMPT-RT patch.  Latency testing of Xenomai3.2+Dovetail with isolating CPU 2,3 ( Xenomai 3.2 on 8MM DDR4 EVK with GPU test case (GLES2/S08_EnvironmentMappingRefraction_Wayland) + iperf3 + 2 ping 65000 size + stress-ng --cpu 2 --io 2 --vm 1 --vm-bytes 256M --metrics-brief )😞 The following is test result by the command (/usr/xenomai/demo/cyclictest -a 2,3 -p 50 -t 5 -m -n -i 1000) root@imx8mmddr4evk:~# /usr/xenomai/demo/cyclictest -a 2,3 -p 50 -t 5 -m -n -i 1000 # /dev/cpu_dma_latency set to 0us policy: fifo: loadavg: 5.96 6.04 6.03 7/155 1349 T: 0 ( 615) P:50 I:1000 C:63448632 Min: 0 Act: 0 Avg: 0 Max: 55 T: 1 ( 616) P:50 I:1500 C:42299087 Min: 0 Act: 0 Avg: 1 Max: 43 T: 2 ( 617) P:50 I:2000 C:31724315 Min: 0 Act: 0 Avg: 1 Max: 51 T: 3 ( 618) P:50 I:2500 C:25379452 Min: 0 Act: 0 Avg: 1 Max: 53 T: 4 ( 619) P:50 I:3000 C:21149543 Min: 0 Act: 0 Avg: 1 Max: 47 //////////////////////////////////////// Update for Yocto L5.10.72 2.2.2  /////////////////////////////////////////////////////////// New release for Yocto release L5.10.72 2.2.2. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git and git checkout xenomai-5.10.72-2.2.2. Updating: 1, Upgrade Xenomai to v3.2.1 Copy xenomai-arm64 to <Yocto folder>/sources/meta-imx/meta-bsp/recipes-kernel, and add the following variable in conf/local.conf before build Image with xenomai enable by command bitbake imx-image-multimedia. XENOMAI_KERNEL_MODE = "cobalt" IMAGE_INSTALL_append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" IMAGE_INSTALL_append += " xenomai" //////////////////////////////////////// Update for Yocto L5.15.71 2.2.0  /////////////////////////////////////////////////////////// New release for Yocto release L5.15.71 2.2.0. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git and git checkout xenomai-5.15.71-2.2.0. Updating: 1, Upgrade Xenomai to v3.2.2 Copy xenomai-arm64 to <Yocto folder>/sources/meta-imx/meta-bsp/recipes-kernel, and add the following variable in conf/local.conf before build Image with xenomai enable by command bitbake imx-image-multimedia. XENOMAI_KERNEL_MODE = "cobalt" IMAGE_INSTALL:append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" IMAGE_INSTALL:append += " xenomai"   //////////////////////////////////////// Update for Yocto L6.1.55 2.2.0  /////////////////////////////////////////////////////////// New release for Yocto release L6.1.55 2.2.0. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git recipes-rtlinux-xenomai -b Linux-6.1.x Updating: 1, Upgrade Xenomai to v3.2.4 and support i.MX93 2, Enable EVL (aka Xenomai 4) for i.MX93 and legacy i.MX(6/7D/8X/8M) Copy recipes-rtlinux-xenomai to <Yocto folder>/sources/meta-imx/meta-bsp/, and add the following variable in conf/local.conf before build Image with xenomai enable by command bitbake imx-image-multimedia. XENOMAI_KERNEL_MODE = "cobalt" IMAGE_INSTALL:append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" IMAGE_INSTALL:append += " xenomai" or XENOMAI_KERNEL_MODE = "evl" IMAGE_INSTALL:append += " libevl"  
查看全文
The document to descript change the u-boot environment variables under the Linux rootfs.  Also provide a demo on i.MX6ull evk of sdcard mirror.  Linux fw_printenv fw_setenv to access U-Boot's environment variables.pdf  --- the document fw_printenv_fw_setenv_demo_iMX6ullevk_L4.14.98_2.0.0_ga.sdcard  --- demo sdcard mirror
查看全文
Guide for Accessing GPIO From UserSpace Summary for Simple GPIO Example - quandry https://community.freescale.com/message/598834#598834
查看全文
  Just sharing some experiences during the development and studying.   Although, it appears some hardwares, it focuses on software to speed up your developing on your  hardware.     杂记共享一下在开发和学习过程中的经验。    虽然涉及一些硬件,但其本身关注软件,希望这些能加速您在自己硬件上的开发。 07/25/2024 iMX secondary boot collection https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX-secondary-boot-collection/ta-p/1916915   07/25/2024 HSM Code-Signing Journey https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/HSM-Code-Signing-Journey/ta-p/1882244 25JUL2024 - add pkcs11 proxy                         HSM Code-Signing Journey_25JUL2024.pdf                          HSM Code-Signing Journey_25JUL2024.txt   06/06/2024 HSM Code-Signing Journey https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/HSM-Code-Signing-Journey/ta-p/1882244     02/07/2024 Device Tree Standalone Compile under Windows https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Device-Tree-Standalone-Compile-under-Windows/ta-p/1855271   02/07/2024 i.MX8X security overview and AHAB deep dive i.MX8X security overview and AHAB deep dive - NXP Community   11/23/2023 “Standalone” Compile Device Tree https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Standalone-Compile-Device-Tree/ta-p/1762373     10/26/2023 Linux Dynamic Debug https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Linux-Dynamic-Debug/ta-p/1746611   08/10/2023 u-boot environment preset for sdcard mirror u-boot environment preset for sdcard mirror - NXP Community   06/06/2023 all(bootloader, device tree, Linux kernel, rootfs) in spi nor demo imx8qxpc0 mek all(bootloader, device tree, Linux kernel, rootfs)... - NXP Community     09/26/2022 parseIVT - a script to help i.MX6 Code Signing parseIVT - a script to help i.MX6 Code Signing - NXP Community   Provide  run under windows   09/16/2022   create sdcard mirror under windows create sdcard mirror under windows - NXP Community     08/03/2022   i.MX8MM SDCARD Secondary Boot Demo https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MM-SDCARD-Secondary-Boot-Demo/ta-p/1500011     02/16/2022 mx8_ddr_stress_test without UI   https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/mx8-ddr-stress-test-without-UI/ta-p/1414090   12/23/2021 i.MX8 i.MX8X Board Reset https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8-i-MX8X-Board-Reset/ta-p/1391130       12/21/2021 regulator userspace-consumer https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/regulator-userspace-consumer/ta-p/1389948     11/24/2021 crypto af_alg blackkey demo crypto af_alg blackkey demo - NXP Community   09/28/2021 u-boot runtime modify Linux device tree(dtb) u-boot runtime modify Linux device tree(dtb) - NXP Community     08/17/2021 gpio-poweroff demo https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/gpio-poweroff-demo/ta-p/1324306         08/04/2021 How to use gpio-hog demo https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-use-gpio-hog-demo/ta-p/1317709       07/14/2021 SWUpdate OTA i.MX8MM EVK / i.MX8QXP MEK https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/SWUpdate-OTA-i-MX8MM-EVK-i-MX8QXP-MEK/ta-p/1307416     04/07/2021 i.MX8QXP eMMC Secondary Boot https://community.nxp.com/t5/i-MX-Community-Articles/i-MX8QXP-eMMC-Secondary-Boot/ba-p/1257704#M45       03/25/2021 sc_misc_board_ioctl to access the M4 partition from A core side sc_misc_board_ioctl to access the M4 partition fr... - NXP Community     03/17/2021 How to Changei.MX8X MEK+Base Board  Linux Debug UART https://community.nxp.com/t5/i-MX-Community-Articles/How-to-Change-i-MX8X-MEK-Base-Board-Linux-Debug-UART/ba-p/1246779#M43     03/16/2021 How to Change i.MX8MM evk Linux Debug UART https://community.nxp.com/t5/i-MX-Community-Articles/How-to-Change-i-MX8MM-evk-Linux-Debug-UART/ba-p/1243938#M40       05/06/2020 Linux fw_printenv fw_setenv to access U-Boot's environment variables Linux fw_printenv fw_setenv to access U-Boot's env... - NXP Community     03/30/2020 i.MX6 DDR calibration/stress for Mass Production https://community.nxp.com/docs/DOC-346065     03/25/2020 parseIVT - a script to help i.MX6 Code Signing https://community.nxp.com/docs/DOC-345998     02/17/2020 Start your machine learning journey from tensorflow playground Start your machine learning journey from tensorflow playground      01/15/2020 How to add  iMX8QXP PAD(GPIO) Wakeup How to add iMX8QXP PAD(GPIO) Wakeup    01/09/2020 Understand iMX8QX Hardware Partitioning By Making M4 Hello world Running Correctly https://community.nxp.com/docs/DOC-345359   09/29/2019 Docker On i.MX6UL With Ubuntu16.04 https://community.nxp.com/docs/DOC-344462   09/25/2019 Docker On i.MX8MM With Ubuntu https://community.nxp.com/docs/DOC-344473 Docker On i.MX8QXP With Ubuntu https://community.nxp.com/docs/DOC-344474     08/28/2019 eMMC5.0 vs eMMC5.1 https://community.nxp.com/docs/DOC-344265     05/24/2019 How to upgrade  Linux Kernel and dtb on eMMC without UUU How to upgrade Linux Kernel and dtb on eMMC without UUU     04/12/2019 eMMC RPMB Enhance and GP https://community.nxp.com/docs/DOC-343116   04/04/2019 How to Dump a GPT SDCard Mirror(Android O SDCard Mirror) https://community.nxp.com/docs/DOC-343079   04/04/2019 i.MX Create Android SDCard Mirror https://community.nxp.com/docs/DOC-343078   04/02/2019: i.MX Linux Binary_Demo Files Tips  https://community.nxp.com/docs/DOC-343075   04/02/2019:       Update Set fast boot        eMMC_RPMB_Enhance_and_GP.pdf   02/28/2019: imx_builder --- standalone build without Yocto https://community.nxp.com/docs/DOC-342702   08/10/2018: i.MX6SX M4 MPU Settings For RPMSG update    Update slide CMA Arrangement Consideration i.MX6SX_M4_MPU_Settings_For_RPMSG_08102018.pdf   07/26/2018 Understand ML With Simplest Code https://community.nxp.com/docs/DOC-341099     04/23/2018:     i.MX8M Standalone Build     i.MX8M Standalone Build.pdf     04/13/2018:      i.MX6SX M4 MPU Settings For RPMSG  update            Add slide CMA Arrangement  Consideration     i.MX6SX_M4_MPU_Settings_For_RPMSG_04132018.pdf   09/05/2017:       Update eMMC RPMB, Enhance  and GP       eMMC_RPMB_Enhance_and_GP.pdf 09/01/2017:       eMMC RPMB, Enhance  and GP       eMMC_RPMB_Enhance_and_GP.pdf 08/30/2017:     Dual LVDS for High Resolution Display(For i.MX6DQ/DLS)     Dual LVDS for High Resolution Display.pdf 08/27/2017:  L3.14.28 Ottbox Porting Notes:         L3.14.28_Ottbox_Porting_Notes-20150805-2.pdf MFGTool Uboot Share With the Normal Run One:        MFGTool_Uboot_share_with_NormalRun_sourceCode.pdf Mass Production with programmer        Mass_Production_with_NAND_programmer.pdf        Mass_Production_with_emmc_programmer.pdf AndroidSDCARDMirrorCreator https://community.nxp.com/docs/DOC-329596 L3.10.53 PianoPI Porting Note        L3.10.53_PianoPI_PortingNote_151102.pdf Audio Codec WM8960 Porting L3.10.53 PianoPI        AudioCodec_WM8960_Porting_L3.10.53_PianoPI_151012.pdf TouchScreen PianoPI Porting Note         TouchScreen_PianoPI_PortingNote_151103.pdf Accessing GPIO From UserSpace        Accessing_GPIO_From_UserSpace.pdf        https://community.nxp.com/docs/DOC-343344 FreeRTOS for i.MX6SX        FreeRTOS for i.MX6SX.pdf i.MX6SX M4 fastup        i.MX6SX M4 fastup.pdf i.MX6 SDCARD Secondary Boot Demo        i.MX6_SDCARD_Secondary_Boot_Demo.pdf i.MX6SX M4 MPU Settings For RPMSG        i.MX6SX_M4_MPU_Settings_For_RPMSG_10082016.pdf Security        Security03172017.pdf    NOT related to i.MX, only a short memo
查看全文
NXP i.MX 8 series of application processors support running ArmV8a 64-bit and ArmV7a 32-bit user space programs.  A Hello World program that prints the size of a long int is cross-compiled as 32-bit and as 64-bit from an Ubuntu host and then each is copied to MCIMX8MQ-EVK and run. Resources: Ubuntu 18.04 LTS Host i.MX 8M Evaluation Kit|NXP  MCIMX8MQ-EVK Linux Binary Demo Files - i.MX 8MQuad EVK L4.9.88_2.0.0_GA release Source Code: Create a file with contents below using your favorite editor, example name hello-sizeInt.c. #include <stdio.h> int main (int argc, char **argv) { printf ("Hello World, size of long int: %zd\n", sizeof (long int)); return 0; }‍‍‍‍‍‍‍ Ubuntu host packages: $ sudo apt-get install -y gcc-arm-linux-gnueabihf $ sudo apt-get install -y gcc-aarch64-linux-gnu‍‍‍‍ Line 1 installs the ArmV7a cross-compile tools: arm-linux-gnueabihf-gcc is used to cross compile on Ubuntu host Line 2 install the ArmV8a cross-compile tools: aarch64-linux-gnu-gcc is used to cross compile on Ubuntu host Create Linux User Space Applications Build each application and use the static option to gcc to include run time libraries. Build ArmV7a 32-bit application: $ arm-linux-gnueabihf-gcc -static hello-sizeInt.c -o hello-armv7a‍-static‍‍ Build ArmV8a 64-bit application: $ aarch64-linux-gnu-gcc -static  hello-sizeInt.c -o hello-armv8a‍-static‍‍ Copy Hello applications from Ubuntu host and run on MCIMX8MQ-EVK Using a SDCARD written with images from L4.9.88_2.0.0 Linux release (see resources for image link), power on EVK with Ethernet connected to network and Serial Console port which was connected to a windows 10 PC. Launched a terminal client (TeraTerm) to access console port. Login credentials: root and no password needed. Since Ethernet was connected a DHCP IP address was acquired, 192.168.1.241 on the EVK.  On the Ubuntu host, secure copy the hello applications to EVK: $ scp hello-armv7a-static root@192.168.1.241:~/ hello-armv7a-static                           100%  389KB   4.0MB/s   00:00    $ scp hello-armv8a-static root@192.168.1.241:~/ hello-armv8a-static                           100%  605KB   4.7MB/s   00:00 ‍‍‍‍‍‍‍‍‍‍ Run: root@imx8mqevk:~# ./hello-armv8a-static Hello World, sizeof long int: 8 root@imx8mqevk:~# ./hello-armv7a-static Hello World, sizeof long int: 4‍‍‍‍‍‍‍‍
查看全文
Ftrace is powerful tracing utility embedded in Linux kernel. It provides a very good method for kernel developer to get insights of the kernel behavior. While official kernel doc for ftrace is somehow long and complex, this document provides a quicker and simpler way to get start with ftrace.
查看全文
This guide is a continuation from our latest Debian 12 Installation Guide for iMX8MM, iMX8MP, iMX8MN and iMX93. Here we will describe the process to install the multimedia and hardware acceleration packages, specifically GPU, VPU and Gstreamer on i.MX8M Mini, i.MX8M Plus and i.MX8M Nano. The guide is based on the one provided by our colleague Build Ubuntu For i.MX8 Series Platform - NXP Community, which requires to previously build an image using Yocto Project with the following distro and image name. Distro name - fsl-imx-wayland Image name – imx-image-multimedia For more information please check our BSP documentation i.MX Yocto Project User’s Guide.   Hardware Requirements Linux Host Computer (Ubuntu 20.04 or later) USB Card reader or Micro SD to SD adapter SD Card Evaluation Kit Board for the i.MX8M Nano, i.MX8M Mini, i.MX8M Plus   Software Requirements Linux Ubuntu (20.04 tested) or Debian for Host Computer BSP version 6.1.55 built with Yocto Project   After built the image we can start the installation by following the steps below:   GPU Installation The GPU Installation consists of copy the files from packages imx-gpu-g2d, imx-gpu-viv, libdrm to the Debian system. As our latest installation guide, we will continue naming “mountpoint” to the directory where Debian system is mounted on our host machine. Regarding the path provided on each step, we put labels <build-path> and <machine> that you will need to change based on your environment. These are the paths that Yocto Project uses to save the packages. However, this could change on your environment and you can find the work directory from each package using the following command: bitbake -e <package-name> | grep ^WORKDIR= This command will show you the absolute path of the package work directory. 1. Install GPU Packages $ sudo cp -Pra <build-path>/tmp/work/armv8a-<machine>-poky-linux/imx-gpu-g2d/6.4.11.p2.2-r0/image/* mountpoint $ sudo cp -Pra <build-path>/tmp/work/armv8a-<machine>-poky-linux/imx-gpu-viv/1_6.4.11.p2.2-aarch64-r0/image/* mountpoint $ sudo cp -Pra <build-path>/tmp/work/armv8a-<machine>-poky-linux/libdrm/2.4.115.imx-r0/image/* mountpoint   2. Install Linux IMX Headers and IMX Parser $ sudo cp -Pra <build-path>/tmp/work/armv8a-<machine>-poky-linux/linux-imx-headers/6.1-r0/image/* mountpoint $ sudo cp -Pra <build-path>/tmp/work/armv8a-poky-linux/imx-parser/4.8.2-r0/image/* mountpoint   3. Use chroot $ sudo LANG=C.UTF-8 chroot mountpoint/ qemu-aarch64-static /bin/bash   4. Install Dependencies $ apt install libudev-dev libinput-dev libxkbcommon-dev libpam0g-dev libx11-xcb-dev libxcb-xfixes0-dev libxcb-composite0-dev libxcursor-dev libxcb-shape0-dev libdbus-1-dev libdbus-glib-1-dev libsystemd-dev libpixman-1-dev libcairo2-dev libffi-dev libxml2-dev kbd libexpat1-dev autoconf automake libtool meson cmake ssh net-tools network-manager iputils-ping rsyslog bash-completion htop resolvconf dialog vim udhcpc udhcpd git v4l-utils alsa-utils git gcc less autoconf autopoint libtool bison flex gtk-doc-tools libglib2.0-dev libpango1.0-dev libatk1.0-dev kmod pciutils libjpeg-dev   5. Create a folder for Multimedia Installation. Here we will clone all the multimedia repositories.  $ mkdir multimedia_packages $ cd multimedia_packages   6. Build Wayland $ git clone https://gitlab.freedesktop.org/wayland/wayland.git $ cd wayland $ git checkout 1.22.0 $ meson setup build --prefix=/usr -Ddocumentation=false -Ddtd_validation=true $ cd build $ ninja install   7. Build Wayland Protocols IMX $ git clone https://github.com/nxp-imx/wayland-protocols-imx.git $ cd wayland-protocols-imx $ git checkout wayland-protocols-imx-1.32 $ meson setup build --prefix=/usr -Dtests=false $ cd build $ ninja install   8. Build Weston $ git clone https://github.com/nxp-imx/weston-imx.git $ cd weston-imx $ git checkout weston-imx-11.0.3 $ meson setup build --prefix=/usr -Dpipewire=false -Dsimple-clients=all -Ddemo-clients=true -Ddeprecated-color-management-colord=false -Drenderer-gl=true -Dbackend-headless=false -Dimage-jpeg=true -Drenderer-g2d=true -Dbackend-drm=true -Dlauncher-libseat=false -Dcolor-management-lcms=false -Dbackend-rdp=false -Dremoting=false -Dscreenshare=true -Dshell-desktop=true -Dshell-fullscreen=true -Dshell-ivi=true -Dshell-kiosk=true -Dsystemd=true -Dlauncher-logind=true -Dbackend-drm-screencast-vaapi=false -Dbackend-wayland=false -Dimage-webp=false -Dbackend-x11=false -Dxwayland=false $ cd build $ ninja install   VPU Installation To install VPU and Gstreamer please follow the steps below: 1. Install firmware-imx $ sudo cp -Pra <build-path>/tmp/work/all-poky-linux/firmware-imx/1_8.22-r0/image/lib/* mountpoint/lib/   2. Install VPU Driver $ sudo cp -Pra <build-path>/tmp/work/armv8a-<machine>-poky-linux/imx-vpu-hantro/1.31.0-r0/image/* mountpoint $ sudo cp -Pra <build-path>/tmp/work/armv8a-<machine>-poky-linux/imx-vpuwrap/git-r0/image/* mountpoint   3. Use chroot $ sudo LANG=C.UTF-8 chroot mountpoint/ qemu-aarch64-static /bin/bash   4. Install dependencies for Gstreamer Plugins $ apt install libgirepository1.0-dev gettext liborc-0.4-dev libasound2-dev libogg-dev libtheora-dev libvorbis-dev libbz2-dev libflac-dev libgdk-pixbuf-2.0-dev libmp3lame-dev libmpg123-dev libpulse-dev libspeex-dev libtag1-dev libbluetooth-dev libusb-1.0-0-dev libcurl4-openssl-dev libssl-dev librsvg2-dev libsbc-dev libsndfile1-dev   5. Change directory to multimedia packages. $ cd multimedia-packages   6. Build gstreamer $ git clone https://github.com/nxp-imx/gstreamer -b lf-6.1.55-2.2.0 $ cd gstreamer $ meson setup build --prefix=/usr -Dintrospection=enabled -Ddoc=disabled -Dexamples=disabled -Ddbghelp=disabled -Dnls=enabled -Dbash-completion=disabled -Dcheck=enabled -Dcoretracers=disabled -Dgst_debug=true -Dlibdw=disabled -Dtests=enabled -Dtools=enabled -Dtracer_hooks=true -Dlibunwind=disabled -Dc_args=-I/usr/include/imx $ cd build $ ninja install   7. Build gst-plugins-base $ git clone https://github.com/nxp-imx/gst-plugins-base -b lf-6.1.55-2.2.0 $ cd gst-plugins-base $ meson setup build --prefix=/usr -Dalsa=enabled -Dcdparanoia=disabled -Dgl-graphene=disabled -Dgl-jpeg=disabled -Dopus=disabled -Dogg=enabled -Dorc=enabled -Dpango=enabled -Dgl-png=enabled -Dqt5=disabled -Dtheora=enabled -Dtremor=disabled -Dvorbis=enabled -Dlibvisual=disabled -Dx11=disabled -Dxvideo=disabled -Dxshm=disabled -Dc_args=-I/usr/include/imx $ cd build $ ninja install   8. Build gst-plugins-good $ git clone https://github.com/nxp-imx/gst-plugins-good -b lf-6.1.55-2.2.0 $ cd gst-plugins-good $ meson setup build --prefix=/usr -Dexamples=disabled -Dnls=enabled -Ddoc=disabled -Daalib=disabled -Ddirectsound=disabled -Ddv=disabled -Dlibcaca=disabled -Doss=enabled -Doss4=disabled -Dosxaudio=disabled -Dosxvideo=disabled -Dshout2=disabled -Dtwolame=disabled -Dwaveform=disabled -Dasm=disabled -Dbz2=enabled -Dcairo=enabled -Ddv1394=disabled -Dflac=enabled -Dgdk-pixbuf=enabled -Dgtk3=disabled -Dv4l2-gudev=enabled -Djack=disabled -Djpeg=enabled -Dlame=enabled -Dpng=enabled -Dv4l2-libv4l2=disabled -Dmpg123=enabled -Dorc=enabled -Dpulse=enabled -Dqt5=disabled -Drpicamsrc=disabled -Dsoup=enabled -Dspeex=enabled -Dtaglib=enabled -Dv4l2=enabled -Dv4l2-probe=true -Dvpx=disabled -Dwavpack=disabled -Dximagesrc=disabled -Dximagesrc-xshm=disabled -Dximagesrc-xfixes=disabled -Dximagesrc-xdamage=disabled -Dc_args=-I/usr/include/imx $ cd build $ ninja install   9. Build gst-plugins-bad $ git clone https://github.com/nxp-imx/gst-plugins-bad -b lf-6.1.55-2.2.0 $ cd gst-plugins-bad $ meson setup build --prefix=/usr -Dintrospection=enabled -Dexamples=disabled -Dnls=enabled -Dgpl=disabled -Ddoc=disabled -Daes=enabled -Dcodecalpha=enabled -Ddecklink=enabled -Ddvb=enabled -Dfbdev=enabled -Dipcpipeline=enabled -Dshm=enabled -Dtranscode=enabled -Dandroidmedia=disabled -Dapplemedia=disabled -Dasio=disabled -Dbs2b=disabled -Dchromaprint=disabled -Dd3dvideosink=disabled -Dd3d11=disabled -Ddirectsound=disabled -Ddts=disabled -Dfdkaac=disabled -Dflite=disabled -Dgme=disabled -Dgs=disabled -Dgsm=disabled -Diqa=disabled -Dkate=disabled -Dladspa=disabled -Dldac=disabled -Dlv2=disabled -Dmagicleap=disabled -Dmediafoundation=disabled -Dmicrodns=disabled -Dmpeg2enc=disabled -Dmplex=disabled -Dmusepack=disabled -Dnvcodec=disabled -Dopenexr=disabled -Dopenni2=disabled -Dopenaptx=disabled -Dopensles=disabled -Donnx=disabled -Dqroverlay=disabled -Dsoundtouch=disabled -Dspandsp=disabled -Dsvthevcenc=disabled -Dteletext=disabled -Dwasapi=disabled -Dwasapi2=disabled -Dwildmidi=disabled -Dwinks=disabled -Dwinscreencap=disabled -Dwpe=disabled -Dzxing=disabled -Daom=disabled -Dassrender=disabled -Davtp=disabled -Dbluez=enabled -Dbz2=enabled -Dclosedcaption=enabled -Dcurl=enabled -Ddash=enabled -Ddc1394=disabled -Ddirectfb=disabled -Ddtls=disabled -Dfaac=disabled -Dfaad=disabled -Dfluidsynth=disabled -Dgl=enabled -Dhls=enabled -Dkms=enabled -Dcolormanagement=disabled -Dlibde265=disabled -Dcurl-ssh2=disabled -Dmodplug=disabled -Dmsdk=disabled -Dneon=disabled -Dopenal=disabled -Dopencv=disabled -Dopenh264=disabled -Dopenjpeg=disabled -Dopenmpt=disabled -Dhls-crypto=openssl -Dopus=disabled -Dorc=enabled -Dresindvd=disabled -Drsvg=enabled -Drtmp=disabled -Dsbc=enabled -Dsctp=disabled -Dsmoothstreaming=enabled -Dsndfile=enabled -Dsrt=disabled -Dsrtp=disabled -Dtinyalsa=disabled -Dtinycompress=enabled -Dttml=enabled -Duvch264=enabled -Dv4l2codecs=disabled -Dva=disabled -Dvoaacenc=disabled -Dvoamrwbenc=disabled -Dvulkan=disabled -Dwayland=enabled -Dwebp=enabled -Dwebrtc=disabled -Dwebrtcdsp=disabled -Dx11=disabled -Dx265=disabled -Dzbar=disabled -Dc_args=-I/usr/include/imx $ cd build $ ninja install   10. Build imx-gst1.0-plugin $ git clone https://github.com/nxp-imx/imx-gst1.0-plugin -b lf-6.1.55-2.2.0 $ cd imx-gst1.0-plugin $ meson setup build --prefix=/usr -Dplatform=MX8 -Dc_args=-I/usr/include/imx $ cd build $ ninja install   11. Exit chroot $ exit   Verify Installation For verification process, boot your target from the SD Card. (Review your specific target documentation) 1. Verify Weston For this verification you will need to be root user. # export XDG_RUNTIME_DIR=/run/user/0 # weston   2. Verify VPU and Gstreamer Use the following Gstreamer pipeline for Hardware Accelerated VPU Encode. # gst-launch-1.0 videotestsrc ! video/x-raw, format=I420, width=640, height=480 ! vpuenc_h264 ! filesink location=test.mp4   Then you can reproduce the file with this command: # gplay-1.0 test.mp4   Finally, you have installed and verified the GPU, VPU and Multimedia packages. Now, you can start testing audio and video applications.
查看全文
Hello, here Jorge. On this post I will explain how to enable MQS1 on i.MX8ULP. As background about how to setup the environment to build the image using Yocto, please take a look on our i.MX Yocto Project User's Guide: Requirements: i.MX 8ULP EVK. Serial console emulator (Tera Term, Putty, etc.). USB Type-C cable. Micro USB cable. Headphones/speakers. Linux PC. Build done in Linux 6.6.23_2.0.0. i.MX8ULP audio subsystem. i.MX 8ULP extends audio capabilities on i.MX 7ULP by adding dedicated DSP cores for voice trigger and audio processing, enabling lower latency and power efficiency to support variety of audio applications. Some of hardware blocks implemented on 8ULP to support audio use cases are the next: Cadence Fusion F1 DSP processor. Cadence HiFi4 DSP processor. PowerQuad hardware accelerator with fixed and floating + FFT. Digital Microphone interface with support of up-to 8 PDM channels. Up-to 8 independent SAI instances. Up-to 2 Medium Quality Sound (MQS). Sony/Philips Digital interface (SPDIF). As is described before, MQS0 and MQS1 are part of real time domain and application domain respectively. I’m going to focus this post on how to enable MQS1 on application domain. Medium Quality Sound (MQS)  This module is basically generates a PWM from PCM audio data. For the major part of typical audio applications will require an external CODEC to deliver the audio quality but, sometimes where the application does not demand this quality, MQS can provide a medium quality audio via GPIO pin that can directly drive the audio output to a speaker or headphone via inexpensive external amplifier/buffer instead of CODEC. The design of the MQS can be described as follows: Input the PCM audio data (from SAI) into a 16-bit register. Up-sample data to match PWM switching frequency. Perform a simple 2nd order Sigma-Delta smooth on the current data versus previous data. Convert the PCM register into a 6-bit PWM width register and output through a GPIO pin.   How to enable it? By default, our BSP does not enable clock for MQS1. This clock is controlled on CGC1 (AD), specifically on MQS1CLK (Multiplexer to select the audio clock connected to the MQS clock input). So, it is needed to modify imx8ulp-clock.h and clk-imx8ulp.c. Please take a look on patch attached at the end of this post to see the modification in drivers easily. These drivers have the definition/configuration for MQS1_SEL in CGC1 and needs to be added as follows: MQS1_SEL definition needs to bed added in imx8ulp-clock.h: #define IMX8ULP_CLK_MQS1_SEL 56 #define IMX8ULP_CLK_CGC1_END 57 MQS1_SEL configuration needs to be added in imx8ulp_clk_cgc1_init of clk-imx8ulp.c: clks[IMX8ULP_CLK_MQS1_SEL] = imx_clk_hw_mux2("mqs1_sel", base + 0x90c, 0, 2, sai45_sels, ARRAY_SIZE(sai45_sels)); Also, it is necessary to configure MQS1 on device tree of i.MX8ULP. Add this in soc: soc@0 of imx8ulp.dtsi: mqs1: mqs@0x29290064 { reg = <0x29290064 0x4>; compatible = "fsl,imx8qm-mqs"; assigned-clocks = <&cgc1 IMX8ULP_CLK_MQS1_SEL>; assigned-clock-parents = <&cgc1 IMX8ULP_CLK_SPLL3_PFD1_DIV1>; clocks = <&cgc1 IMX8ULP_CLK_MQS1_SEL>, <&cgc1 IMX8ULP_CLK_MQS1_SEL>; clock-names = "core", "mclk"; status = "disabled"; }; And create a new device tree, in this case is going to be named imx8ulp-evk-mqs.dts and is as follows: #include "imx8ulp-evk.dts" / { sound-simple-mqs { compatible = "simple-audio-card"; simple-audio-card,name = "imx-simple-mqs"; simple-audio-card,frame-master = <&sndcpu>; simple-audio-card,bitclock-master = <&sndcpu>; simple-audio-card,dai-link@0 { format = "left_j"; sndcpu: cpu { sound-dai = <&sai4>; }; codec { sound-dai = <&mqs1>; }; }; }; }; &cgc1 { assigned-clock-rates = <24576000>; }; &iomuxc1 { pinctrl_mqs1: mqs1grp { fsl,pins = < MX8ULP_PAD_PTF7__MQS1_LEFT 0x43 >; }; }; &mqs1 { #sound-dai-cells = <0>; pinctrl-names = "default"; pinctrl-0 = <&pinctrl_mqs1>; status = "okay"; }; &sai4 { #sound-dai-cells = <0>; assigned-clocks = <&cgc1 IMX8ULP_CLK_SAI4_SEL>; assigned-clock-parents = <&cgc1 IMX8ULP_CLK_SPLL3_PFD1_DIV1>; status = "okay"; }; Let’s apply these changes on our BSP, in my case I’m going to create a new layer in Yocto to add these modifications with a patch that can be found at the end on this post, here the steps: Install essential Yocto Project host packages: $ sudo apt install gawk wget git diffstat unzip texinfo gcc build-essential chrpath socat cpio python3 python3-pip python3-pexpect xz-utils debianutils iputils-ping python3-git python3-jinja2 python3-subunit zstd liblz4-tool file locales libacl1 Install the “repo” utility: $ mkdir ~/bin $ curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo $ chmod a+x ~/bin/repo $ export PATH=~/bin:$PATH Set up Git: $ git config --global user.name "Your Name" $ git config --global user.email "Your Email" $ git config –list Download the i.MX Yocto Project Community BSP recipe layers and create build folder: $ mkdir imx-yocto-bsp $ cd imx-yocto-bsp $ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-scarthgap -m imx-6.6.23-2.0.0.xml $ repo sync $ DISTRO=fsl-imx-wayland MACHINE=imx8ulp-lpddr4-evk source imx-setup-release.sh -b 8ulp_build Create the new layer: $ cd ~/imx-yocto-bsp/sources $ bibake-layers create-layer meta-mqs $ cd meta-mqs conf/layer.conf should be as follows: BBPATH .= ":${LAYERDIR}" BBFILES += "${LAYERDIR}/recipes-*/*/*.bb \ ${LAYERDIR}/recipes-*/*/*.bbappend" BBFILE_COLLECTIONS += "meta-mqs" BBFILE_PATTERN_meta-mqs = "^${LAYERDIR}/" BBFILE_PRIORITY_meta-mqs = "6" LAYERSERIES_COMPAT_meta-mqs = "nanbield" Let’s change the recipe: $ sudo rm -r recipes-example $ mkdir -p recipes-kernel/linux/files 0001-8ULP-MQS-Enable.patch should be copied to ~/imx-yocto-bsp/sources/meta-mqs/recipes-kernel/linux/files Add an append (on this case is called “linux-imx_%.bbappend”)to change the recipe with next content: FILESEXTRAPATHS:prepend := "${THISDIR}/files:" SRC_URI += "file:// 0001-8ULP-MQS-Enable.patch " addtask copy_dts after do_unpack before do_prepare_recipe_sysroot do_copy_dts () { if [ -n "${DTS_FILE}" ]; then if [ -f ${DTS_FILE} ]; then echo "do_copy_dts: copying ${DTS_FILE} in ${S}/arch/arm64/boot/dts/freescale" cp ${DTS_FILE} ${S}/arch/arm64/boot/dts/freescale/ fi fi } The next step is add the layer and build the image: $ cd ~/imx-yocto-bsp/8ulp_build $ bitbake-layers add-layer ~/imx-yocto-bsp/sources/meta-mqs Confirm that the layer has been added: $ bitbake-layers show-layers Build the image: $ bitbake imx-image-multimedia i.MX8ULP EVK limitations The i.MX8ULP has the next MQS1 pins available: But, in the EVK board, the mayor part of these pins are used for other functions such as: - Push button: - MIPI DSI:  - Etc… So, take the output signal of MQS1 pins of EVK board is difficult, in this article, I’m going to configure PTF7 only (MQS1_left) for practicality. If you are working with this board and you need to use these pins for MQS function you will need to manipulate the traces and take the required signals. If you are designing a custom board, planning is essential to avoid this issue. Flash the board. One the build has been finished, we will have the necessary files to flash the board and test it. If you are not too familiarized with this process I suggest you take a look on this post. First, put the board in serial download mode changing the boot configuration switches on the board:   The next step is connecting the power cable, micro-USB cable on the debug port and USB-C type cable to USB0 connector on the board. Then, turn-on the board and run the next command in terminal of build directory: uuu -b emmc_all imx-boot-imx8ulpevk-sd.bin-flash_singleboot_m33 imx-image-multimedia-imx8ulpevk.wic Now, power-off the board, change the boot mode to single boot-eMMC and power it on to test it. Test MQS1 in i.MX8ULP. To test MQS1 it is needed to change the device tree we created, we can do it with the next commands in U-boot: u-boot=> setenv fdtfile imx8ulp-evk-mqs.dtb u-boot=> saveenv u-boot=> boot Now we can test MQS1 on i.MX8ULP EVK, let's confirm that the clock is active in MQS module with the next command: $ cat /sys/kernel/debug/clk/clk_summary -n As you can see mqs1_sel is active and running at 24576000 Hz: And the card appears if we run the next command: $ aplay -l To play audio through MQS we can do it as any sound card: $ speaker-test -D sysdefault:CARD=imxsimplemqs -c 2 -f 48000 -F S16_LE -t pink -P 3 The signal should look like this in the pin output: And like this after a filter, for example the filter used in i.MX93 EVK.   With this post we have been able check the general operation of MQS, configure and compile the image with the required changes to enable MQS1 on EVK board and measure the output on the board. There is a considerable limitation on EVK board since we cannot test left and right outputs without intervene the base board, but this can be helpful as a reference to who would like to use this audio output on i.MX8ULP processor. Best regards. References. Yocto Project customization guide - NXP Community How to add a new layer and a new recipe in Yocto - NXP Community Flashing Linux BSP using UUU - NXP.  i.MX8ULP reference manual. Embedded Linux Projects Using Yocto Project Cookbook.
查看全文
This document is about to build an image by Yocto , and it will disable a function that normal user can’t use command line of “ su ”.
查看全文
The following steps allow to make use of device tree overlay files, a definition of device tree overlay provided by kernel.org is the next:  "A Devicetree’s overlay purpose is to modify the kernel’s live tree, and have the modification affecting the state of the kernel in a way that is reflecting the changes. Since the kernel mainly deals with devices, any new device node that result in an active device should have it created while if the device node is either disabled or removed all together, the affected device should be deregistered." Knowing that, in this post will be used as an example the baseboard "i.MX 93 EVK" and will be added with device tree overlay an LVDS panel, adding an automatic detection from u-boot, and will be used a host with linux version Ubuntu 20.04.2. Note: It only works for linux kernel version 6.6.3-nanbield onward. Linux device-tree overlay from linux-imx   This section explains all about device tree overlay compilation and building, to create a .dtso file, the equivalent of .dts for overlays, adding some difference between them, using as base the linux-imx repository. It can be downloaded from the following repository:   git clone https://github.com/nxp-imx/linux-imx.git -b <branch version>   Branch version used by this post "lf-6.6.3-1.0.0". Device tree source overlay (.dtso)    It can be similar to a device tree source (.dts) but it had little difference between them, there are some difference in the next list: There's another type of files to be included, if is used pinmux it's necessary adding it with "#include "imx93-pinfunc.h"" and libraries from dt-bindings, it depends on the type of device tree to implement "#include <dt-bindings/<library>>" At initialization it needs to add: "/dts-v1/;"  "/plugin/;" Addition of "fragment" nodes, it allow override parts of a device tree,  it can be a specific node or create a new node. following structure it's the structure of a fragment:   { /* ignored properties by the overlay */ fragment@0 { /* first child node */ target=<phandle>; /* phandle target of the overlay */ or target-path="/path"; /* target path of the overlay */ __overlay__ { property-a; /* add property-a to the target */ node-a { /* add to an existing, or create a node-a */ ... }; }; } fragment@1 { /* second child node */ ... }; /* more fragments follow */ }   kernel.org Overlays can't delete a property or a node when it's applied, so can't be used "/delete-node/" nor "/delete-prop/", but it can be added to the node "status = "disabled";" to disable it.  Using as an example the file imx93-11x11-evk-boe-wxga-lvds-panel.dts located in the previous repository file direction <linux-imx path>/arch/arm64/boot/dts/freescale/ using it as a base tree:   // SPDX-License-Identifier: (GPL-2.0+ OR MIT) /* * Copyright 2022 NXP */ #include "imx93-11x11-evk.dts" / { lvds_backlight: lvds_backlight { compatible = "pwm-backlight"; pwms = <&adp5585pwm 0 100000 0>; enable-gpios = <&adp5585gpio 8 GPIO_ACTIVE_HIGH>; power-supply = <&reg_vdd_12v>; status = "okay"; brightness-levels = < 0 1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31 32 33 34 35 36 37 38 39 40 41 42 43 44 45 46 47 48 49 50 51 52 53 54 55 56 57 58 59 60 61 62 63 64 65 66 67 68 69 70 71 72 73 74 75 76 77 78 79 80 81 82 83 84 85 86 87 88 89 90 91 92 93 94 95 96 97 98 99 100>; default-brightness-level = <80>; }; ... }; ... &adv7535 { status = "disabled"; }; ...   imx93-11x11-evk-boe-wxga-lvds-panel.dts Using the previous points and making use of fragments, if we want adapt the node lvds_backlight as fragment, it will be  added in the section of overlay, and adding it to a target-path "/":   #include <dt-bindings/interrupt-controller/irq.h> #include "imx93-pinfunc.h" #include <dt-bindings/gpio/gpio.h> /dts-v1/; /plugin/; / { fragment@0 { target-path = "/"; __overlay__ { lvds_backlight: lvds_backlight { compatible = "pwm-backlight"; pwms = <&adp5585pwm 0 100000 0>; enable-gpios = <&adp5585gpio 8 GPIO_ACTIVE_HIGH>; power-supply = <&reg_vdd_12v>; status = "okay"; brightness-levels = < 0 1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31 32 33 34 35 36 37 38 39 40 41 42 43 44 45 46 47 48 49 50 51 52 53 54 55 56 57 58 59 60 61 62 63 64 65 66 67 68 69 70 71 72 73 74 75 76 77 78 79 80 81 82 83 84 85 86 87 88 89 90 91 92 93 94 95 96 97 98 99 100>; default-brightness-level = <80>; }; }; }; ... };   imx93-11x11-evk-test-lvds-panel.dtso In the case of adding a property to an existing node, it will look in the following way using as example the node adv7535.   ... / { ... fragment@2 { target = <&adv7535>; __overlay__ { status = "disabled"; }; }; ... };   imx93-11x11-evk-boe-wxga-lvds-panel.dts At the end of this post, will be attach the complete file used for LVDS panel named as imx93-11x11-evk-test-lvds-panel.dtso Build device tree blob for overlay (dtbo)   To compile the previous .dtso it's necessary to include it to linux-imx repository, linux device tree overlay was included in BSP from version 6.6.3-nanbield onward in Makefile, so it's only necessary adding it as files to be compiled as .dtso, at the end of the post will be a patch file named as linux-imx-makefile.patch to add LVDS-panel to Makefile from branch lf-6.6.3-1.0.0 Add previously file imx93-11x11-evk-test-lvds-panel.dtso to path <linux-imx path>/arch/arm64/boot/dts/freescale/ Add imx93-11x11-evk-test-lvds-panel.dtso as file to be compiled in Makefile, it is located in the next path <linux-imx path>/arch/arm64/boot/dts/freescale/Makefile, it can be added with the next sentence format: <overlay without extension>-dtbs := <file to be overlayed>.dtb <overlay>.dtbo Example of how to add LVDS panel to makefile  imx93-11x11-evk-test-lvds-panel-dtbs := imx93-11x11-evk.dtb imx93-11x11-evk-test-lvds-panel.dtbo Makefile From main path, make the configuration to be compiled with the following bash command: $ cd <linux-imx path>/ $ make -j$(nproc --all) ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- imx_v8_defconfig​ Compile overlay to use $ make -j $(nproc --all) ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- freescale/<overlay>.dtbo​ as example for LVDS panel $ make -j $(nproc --all) ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- freescale/imx93-11x11-evk-test-lvds-panel.dtbo It will compile the device tree blob overlay to use. Copy .dtbo generated in memory used by i.MX 93, it can be sending it from scp. scp ./​<overlay>.dtbo​ root@<ip>:/run/media/<memory section used> u-boot   This section explain the procedure to load a device tree overlay, it will be from u-boot explaining commands used and using the LVDS panel as an example. Before applying overlay   Before applying, it's necessary had a device tree loaded so looking around in the process of booting in a i.MX 93 from u-boot, this process is defined by the enviroment variable "bsp_bootcmd" that calls the variable mmcboot, and looking what does these variables, it can be look in the following sentence:    bsp_bootcmd=echo Running BSP bootcmd ...; mmc dev ${mmcdev}; if mmc rescan; then if run loadbootscript; then run bootscript; else if test ${sec_boot} = yes; then if run loadcntr; then run mmcboot; else run netboot; fi; else if run loadimage; then run mmcboot; else run netboot; fi; fi; fi; fi; mmcboot=echo Booting from mmc ...; run mmcargs; if test ${sec_boot} = yes; then if run auth_os; then run boot_os; else echo ERR: failed to authenticate; fi; else if test ${boot_fit} = yes || test ${boot_fit} = try; then bootm ${loadaddr}; else if run loadfdt; then run boot_os; else echo WARN: Cannot load the DT; fi; fi;fi;   but reducing it in a normal situation, ignoring if else case and echoes, it can be simplify to:   mmc dev ${mmcdev}; run loadimage; run mmcargs; run loadfdt; run boot_os;   the device tree is load is in the section "run loadfdt" with fatload in his definition:   loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr_r} ${fdtfile}   So, it's necessary to applying device tree overlay after "run loadfdt". How to apply an overlay   To load correctly an overlay it's necessary to following some steps: Load flattened device tree (fdt). (executed by loadfdt) Configure fdt address.  In some cases it's necessary to expand fdt memory size Load overlay Apply overlay The full sentence to apply it, it's the following u-boot command:   u-boot=> setexpr fdtovaddr ${fdt_addr} + 0xF0000; setexpr fdt_buffer 16384; fdt addr ${fdt_addr} && fdt resize ${fdt_buffer}; fatload mmc ${mmcdev}:${mmcpart} ${fdtovaddr} <overlay>.dtbo && fdt apply ${fdtovaddr};   First of all, setexpr it's just to create a new variable, in this case these variable is an integer. Spliting the previously command we can found the steps to applying it. "fdt addr ${fdt_addr};" used to configure fdt address, and point to the space of memory previously charged. "fdt resize ${fdt_buffer};" expand fdt memory size, is used as a value 16384 just to get the enough space to charge dtbo, this number was related with 2 14 "fatload mmc ${mmcdev}:${mmcpart} ${fdtovaddr} <overlay>.dtbo" Load device tree overlay using fdovaddr, that is fdt_addr adding an offset of memory space.  "fdt apply ${fdtovaddr};" apply device tree overlay Remembering about load overlay needs to be executed after loadfdt, it's possible to save the previous command to a variable and executing it after loadfdt with setexpr, in this case using as example lvds test.   u-boot=> setenv loadoverlay "setexpr fdtovaddr ${fdt_addr} + 0xF0000; setexpr fdt_buffer 16384; fdt addr $\{fdt_addr\} && fdt resize $\{fdt_buffer\}; fatload mmc $\{mmcdev\}:$\{mmcpart\} $\{fdtovaddr\} imx93-11x11-evk-test-lvds-panel.dtbo && fdt apply $\{fdtovaddr\};"   and modifying mmcboot with loadoverlay after loadfdt   u-boot=> setenv mmcboot "run mmcargs; run loadfdt; run loadoverlay; run boot_os;"   to save the environment variables created, it can be saved from u-boot wit the following command.   u-boot=> saveenv   At the end, boot imx93   u-boot=> boot   The LVDS panel should be working using the original dtb (imx93-11x11-evk.dtb) applied the overlay. Automatize u-boot LVDS Panel   This section explain how can be automatize the u-boot load overlay using an LVDS panel, it can vary depending the device to used for, the method used is detecting it in u-boot initialization and if found any device it will generate an environment variable. All the steps was using as a base uboot-imx repository, it can be downloaded from the following repository, at the end of this post will be a patch with the changes.   git clone https://github.com/nxp-imx/uboot-imx.git -b <branch version>   Branch version used "lf-6.6.3-1.0.0". Base   Knowing more about LVDS Panel used by imx93 it's really hard know more information about registers, so in this example will be limited to detect that is connected the address to a corresponding bus from touch controller.  To know i2c address and bus used by LVDS panel it was used searching it from the original device tree in the next section:   &lpi2c1 { exc80h60: touch@2a { compatible = "eeti,exc80h60"; reg = <0x2a>; pinctrl-names = "default"; pinctrl-0 = <&pinctrl_ctp_int>; /* * Need to do hardware rework here: * remove R131, short R181 */ interrupt-parent = <&gpio2>; interrupts = <21 IRQ_TYPE_LEVEL_LOW>; reset-gpios = <&pcal6524 17 GPIO_ACTIVE_HIGH>; status = "okay"; }; };   imx93-11x11-evk-boe-wxga-lvds-panel.dts Previous node is related with touch controller from LVDS using lpi2c1, the first channel of i2c corresponding to i2c bus 0, and the register used express the address used to be detected by device tree, in this case was the address 0x2A. u-boot generating a trigger   About how it can be detected touch controller from u-boot, this procedure use a function named as "board_late_init", it can be found by his definition from u-boot readme:   Board initialization settings: ------------------------------ During Initialization u-boot calls a number of board specific functions to allow the preparation of board specific prerequisites, e.g. pin setup before drivers are initialized. To enable these callbacks the following configuration macros have to be defined. Currently this is architecture specific, so please check arch/your_architecture/lib/board.c typically in board_init_f() and board_init_r(). - CONFIG_BOARD_EARLY_INIT_F: Call board_early_init_f() - CONFIG_BOARD_EARLY_INIT_R: Call board_early_init_r() - CONFIG_BOARD_LATE_INIT: Call board_late_init()   u-boot README In the case of i.MX 93 this function can be found in the next path <u-boot path>/board/freescale/imx93_evk/imx93_evk.c. Using the library included, "uclass.h", it will create a function that, if detect in the bus 0 (LVDS i2c bus) the address 0x2A (i2c LVDS address), it will create an environment variable with the overlay used, it can be set with the function env_set(<String with the name of the variable>, <String with the content of the variable>), the following function can detect and create the environment variable mentioned, creating it with the name "device-tree-overlay" with the content "lvds-panel".   #define LVDS_TOUCH_I2C_BUS 0 #define LVDS_TOUCH_I2C_ADDR 0x2A static void detect_display_connected(void) { struct udevice *bus = NULL; struct udevice *i2c_dev = NULL; int ret; ret = uclass_get_device_by_seq(UCLASS_I2C, LVDS_TOUCH_I2C_BUS, &bus); if (ret) { printf("%s: Can't find bus\n", __func__); } else { ret = dm_i2c_probe(bus, LVDS_TOUCH_I2C_ADDR, 0, &i2c_dev); if (ret) { printf("%s: Can't find device id=0x%x\n", __func__, LVDS_TOUCH_I2C_ADDR); } else { env_set("device-tree-overlay", "lvds-panel"); } } }   imx93_evk.c At the end, add this function to the previously mention, named as board_late_init, in the section CONFIG_ENV_VARS_UBOOT_RUNTIME_CONFIG, like the following snipped from code:   int board_late_init(void) { #ifdef CONFIG_ENV_IS_IN_MMC board_late_mmc_env_init(); #endif env_set("sec_boot", "no"); #ifdef CONFIG_AHAB_BOOT env_set("sec_boot", "yes"); #endif #ifdef CONFIG_ENV_VARS_UBOOT_RUNTIME_CONFIG env_set("board_name", "11X11_EVK"); env_set("board_rev", "iMX93"); detect_display_connected(); #endif return 0; }   imx93_evk.c Now, when it's starting u-boot after flashing, it will generate the environment variable as trigger if something it's connected with that i2c address, else it doesn't do anything. u-boot applying device tree overlay through event   As was explained in the section "How to apply device tree overlay", applying the device tree overlay automatically after configure the trigger it's easy, just adding an if/else case for this example, it can be more ways to applying it, even it's possible adding more of one device tree overlay, but in this example will load one.  Using u-boot command "test -e <environment variable>" it will detect if exist this environment variable, adding it to an if/else sentence it can create the event and applying the overlay if was detected or not, for this solution will be added this if/else as input if exists loadoverlay variable with the following structure:   u-boot=> if test -e ${device-tree-overlay}; then <case exists device-tree-overlay variable> else <case doesn't exists device-tree-overlay variable>; fi;   adding it to loadoverlay, it will be written like the following command:   u-boot=> setenv loadoverlay "if test -e ${device-tree-overlay}; then setexpr fdtovaddr ${fdt_addr} + 0xF0000; setexpr fdt_buffer 16384; fdt addr ${fdt_addr} && fdt resize $\{fdt_buffer\}; fatload mmc ${mmcdev}:${mmcpart} $\{fdtovaddr\} imx93-11x11-evk-test-lvds-panel.dtbo; fdt apply $\{fdtovaddr\} ; else echo no overlay; fi;"   A no recommended method it's that it can be saved the environment, and changing mmcboot variable with the following command:   u-boot=> setenv mmcboot "run mmcargs; run loadfdt; run loadoverlay; run boot_os;"; saveenv;   The problem about just saving it, it still necessary compile u-boot to load auto-detection of LVDS panel and flashing, another way to add the event trigger, it's adding it to u-boot as initial environment variable, it can be added in the header file of imx93, it is located in the next path <u-boot path>/include/configs/imx93_evk.h, line number 60, it can be added with the same string but it's recommended follow the same structure, like the following definition:   /* Initial environment variables */ #define CFG_EXTRA_ENV_SETTINGS \ ... "loadoverlay=echo loading overlays from mmc ...; " \ "if test -e ${device-tree-overlay}; then " \ "setexpr fdtovaddr ${fdt_addr} + 0xF0000; " \ "setexpr fdt_buffer 16384; " \ "fdt addr ${fdt_addr} && fdt resize ${fdt_buffer}; " \ "fatload mmc ${mmcdev}:${mmcpart} ${fdtovaddr} imx93-11x11-evk-test-lvds-panel.dtbo && fdt apply ${fdtovaddr}; " \ "else " \ "echo no overlay; " \ "fi;\0" \ ...   imx93_evk.h it also it's necessary to change mmcboot environment variable adding loadoverlay after executing loadfdt.    /* Initial environment variables */ #define CFG_EXTRA_ENV_SETTINGS \ .. "mmcboot=echo Booting from mmc ...; " \ "run mmcargs; " \ "if test ${sec_boot} = yes; then " \ "if run auth_os; then " \ "run run boot_os; " \ "else " \ "echo ERR: failed to authenticate; " \ "fi; " \ "else " \ "if test ${boot_fit} = yes || test ${boot_fit} = try; then " \ "bootm ${loadaddr}; " \ "else " \ "if run loadfdt; then " \ "run loadoverlay; " \ "run boot_os; " \ "else " \ "echo WARN: Cannot load the DT; " \ "fi; " \ "fi;" \ "fi;\0" \ ...   imx93_evk.h To build u-boot, copy the following commands in main path from u-boot   $ cd <u-boot path> $ make -j $(nproc --all) clean PLAT=imx93 CROSS_COMPILE=aarch64-linux-gnu- $ make -j $(nproc --all) ARCH=arm CROSS_COMPILE=aarch64-linux-gnu- imx93_11x11_evk_defconfig $ make -j $(nproc --all) PLAT=imx93 CROSS_COMPILE=aarch64-linux-gnu-   generating the files u-boot.bin and u-boot-spl.bin located in <uboot-imx path>/ and <uboot-imx path>/spl Build imx-boot image using imx-mkimage   To build the binary necessary to flash to iMX 93 EVK it's necessary build a file named as flash.bin, it can building using the next repository using the branch used for this example:    $ git clone https://github.com/nxp-imx/imx-mkimage.git -b lf-6.6.3_1.0.0   to build imx-boot image it's necessary adding some files to the path <imx-mkimage path>/iMX93, including 2 generated by u-boot, u-boot.bin and u-boot-spl.bin, move these files to iMX93 directory.   $ cp <uboot-imx path>/u-boot.bin <uboot-imx path>/spl/u-boot-spl.bin <imx-mkimage path>/iMX93/   follow the steps from imx linux users guide section 4.5.13 and imx linux release notes section 1.2 to build flash.bin, as an example of compile, there's the steps to compile for imx93. Get mx93a1-ahab-container.img $ wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-sentinel-0.11.bin $ chmod +x firmware-sentinel-0.11.bin $ ./firmware-sentinel-0.11.bin $ cp firmware-sentinel-0.11/mx93a1-ahab-container.img <imx-mkimage path>/iMX93/​ Get lpddr4_imem_1d_v202201.bin, lpddr4_dmem_2d_v202201.bin, lpddr4_imem_1d_v202201.bin and lpddr4_imem_2d_v202201.bin $ wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.23.bin $ chmod +x firmware-imx-8.23.bin $ ./firmware-imx-8.23.bin $ cp firmware-imx-8.23/firmware/ddr/synopsys/lpddr4_dmem_1d_v202201.bin firmware-imx-8.23/firmware/ddr/synopsys/lpddr4_dmem_2d_v202201.bin firmware-imx-8.23/firmware/ddr/synopsys/lpddr4_imem_1d_v202201.bin firmware-imx-8.23/firmware/ddr/synopsys/lpddr4_imem_2d_v202201.bin <imx-mkimage path>/iMX93/​ Get bl31.bin $ git clone https://github.com/nxp-imx/imx-atf.git -b lf-6.6.3-1.0.0 $ cd imx-atf $ make -j $(nproc --all) PLAT=imx93 CROSS_COMPILE=aarch64-linux-gnu- $ cp <imx-atf path>/build/imx93/release/bl31.bin <imx-mkimage path>/iMX93​ Compile flash.bin from imx-mkimage $ cd <imx-mkimage path>/ $ make SOC=iMX9 REV=A1 flash_singleboot​ it will generate the binary flash.bin located in the path <imx-mkimage path>/iMX93/flash.bin. Flashing u-boot   Flashing just u-boot image using flash.bin, will be used uuu.exe, it can be downloaded from the his repositroy, try using the most recent version taged as "Latest"    https://github.com/nxp-imx/mfgtools/releases   make sure is using i.MX 93 EVK in boot mode download and connect it to your host from download USB port, using uuu.exe run the next code:   .\uuu.exe -b emmc .\flash.bin   or it can be flashed the full image with flash.bin binary.   .\uuu.exe -b emmc_all .\flash.bin ..\uuu\imx-image-full-imx93evk.wic   after that, starting be will using the created u-boot environment. Result   Inside u-boot, when it's connected the LVDS panel, it will create the variable named "device-tree-overlay" and will be charged automatically LVDS panel overlay, enabling it, if not it will working normally using DSI as output. Note: Ensure to have imx93-11x11-evk-test-lvds-panel.dtbo in memory. Reference   Device tree overlay: https://docs.kernel.org/devicetree/overlay-notes.html  
查看全文
The user interface has limited the use of the tool GUI Guider. Getting an interaction only through a mouse or touchscreen can be enough for some use cases. However, sometimes the use case requires to go beyond its limitations. This video/appnote explores the possibility of integrating voice by creating a bridge between a speech recognition technology, such as VIT, and the interface creator GUI Guider. It uses a universal way to link all the voice recognition commands and a wakeword to any interaction created by GUI Guider. The following video shows the steps necessary to create that connection by creating the voice recognition using VIT voice commands and wakewords, create an interface of GUI Guider using a template, how to connect between them using the board i.MX 93 evk and testing it. For more information consult the following links AppNote HTML: https://docs.nxp.com/bundle/AN14270/page/topics/abstract.html?_gl=1*1glzg9k*_ga*NDczMzk4MDYuMTcxNjkyMDI0OA..*_ga_WM5LE0KMSH*MTcxNjkyMDI0OC4xLjEuMTcxNjkyMDcyMy4wLjAuMA AppNote PDF: https://www.nxp.com/docs/en/application-note/AN14270.pdf Associated File: AN14270SW  
查看全文
  Some customers want to expose their i3c device on the /dev, In order to develop their i3c APP or operation the i3c device like I2C. But in our default BSP code, we do not support this feature for I3C device, This article will introduce how to make the i3c device expose to the user space. Board : i.MX 93 EVK BSP Version : lf-6.1.55-2.2.0 I3C device : LSM6DSOXTR Step 1 : Rework the i.MX93 EVK Board, Install the R1010.      Step 2 : Apply the add_i3c_device_to_dev.patch file to the linux kernel code              Command : git apply add_i3c_device_to_dev.patch Step 3 : Re-compile the kernel Image file.              Command : make imx_v8_defconfig                                  make Step 4 : Boot your board with "imx93-11x11-evk-i3c.dtb" file and see if you can see the I3C device on the /dev directory. Result : We can see the i3c device is appeared in /dev directory, The i2c-8 is an i2c device mounted to the i3c bus. The i3c is backward compatible with i2c device. It will simulate the I2C signal loading i2c device.                 PS : You can also use the i2ctool detect i2c-8 device. As shown in the following picture:   Note : If you need the patch file, Please contact me any time for free.
查看全文
-- DTS for gpio wakeup   // SPDX-License-Identifier: (GPL-2.0+ OR MIT) /*  * Copyright 2022 NXP  */   #include "imx93-11x11-evk.dts"   / {         gpio-keys {                 compatible = "gpio-keys";                 pinctrl-names = "default";                 pinctrl-0 = <&pinctrl_gpio_keys>;                   power {                   label = "GPIO Key Power";                   linux,code = <KEY_POWER>;                   gpios = <&gpio2 7 GPIO_ACTIVE_LOW>;                   wakeup-source;                   debounce-interval = <20>;                   interrupt-parent = <&gpio2>;                   interrupts = <7 IRQ_TYPE_LEVEL_LOW>;                 };         }; };   &iomuxc {         pinctrl_gpio_keys: gpio_keys_grp {                 fsl,pins = <                         MX93_PAD_GPIO_IO07__GPIO2_IO07  0x31e                 >;         }; }; -- testing the switch GPIO  First check if your gpio dts configuration to make it act as a switch works or not After executing the command - 'evtest /dev/input/event1' Trigger an interrupt by connecting GPIO2 7 to GND, as soon as you do that, you will receive Event logs such as below:- This shows that your dts configuration for GPIO works.     -- Verify the interrupt         -- Go to sleep and then connect the GPIO to GND to trigger a wakeup, in the logs we see that kernel exits the suspend mode    
查看全文