Sometimes an external Linux Kernel Module is needed. This document describes the steps to create your own out-of-tree kernel module recipe for Yocto.
In order to do this, the document will guide you through the process by adding a Linux kernel module called pmu_user.ko to the avs-image for the i.MX 8M boards. These steps should apply for similar incorporation of any kernel to Yocto images.
Go to the directory where you have your Yocto build environment ready and create a new meta layer in Yocto:
cd <imx-yocto-bsp>/<build dir>
#Create a new meta layer and give the directory a descriptive name
bitbake-layers create-layer ../layers/meta-pmu
#Go to layer directory
cd ../layers/meta-pmu
There should be already a layer example created by default. We will remove the recipes-example directory and create a new one with the corresponding name of the kernel module we are incorporating:
.
├── conf
│ └── layer.conf
├── COPYING.MIT
├── README
└── recipes-example
└── example
└── example_0.1.bb
3 directories, 4 filesrm -rf recipes-example/
mkdir recipes-pmu
The poky git repository of Yocto Project provides a template for out-of-tree modules. The easiest way to incorporate a kernel module for the first time is by using this resource.
Let's go to the created directory and copy the hello-mod.bb recipe available at poky/meta-skeleton/recipes-kernel/hello-mod/. This is the template from which you can create your own out-of-tree Linux Kernel module recipe.
cd recipes-pmu
# Copy the template to the recipes-pmu directory
cp -fvR ../../../sources/poky/meta-skeleton/recipes-kernel/hello-mod .
Now you should see the following directories and files inside recipes-pmu:
.
└── hello-mod
├── files
│ ├── COPYING
│ ├── hello.c
│ └── Makefile
└── hello-mod_0.1.bb
2 directories, 4 files
You can store any source files, patches, or other files as necessary for building the module in the files directory. For this example, no additional files were needed.
Before anything else, we should change the name of hello-mod directory to pmu-mod and the name of hello-mod_0.1.bb to pmu-mod_0.1.bb:
mv hello-mod/ pmu-mod/
cd pmu-mod
mv hello-mod_0.1.bb pmu-mod_0.1.bb
Now, let's see what's inside the pmu-mod_0.1.bb file:
SUMMARY = "Example of how to build an external Linux kernel module"
DESCRIPTION = "${SUMMARY}"
LICENSE = "GPLv2"
LIC_FILES_CHKSUM = "file://COPYING;md5=12f884d2ae1ff87c09e5b7ccc2c4ca7e"
inherit module
SRC_URI = "file://Makefile \
file://hello.c \
file://COPYING \
"
S = "${WORKDIR}"
# The inherit of module.bbclass will automatically name module packages with
# "kernel-module-" prefix as required by the oe-core build environment.
RPROVIDES_${PN} += "kernel-module-hello"
The most important line is the inherit module, which tells the bitbake command how to properly build the kernel module. Notice that there is no do_compile or do_install needed.
For best practices, create a new git repository for the kernel module and move the makefile and COPYING files to it. Also, add the necessary source files for the kernel module. For the pmu_user.ko we need to include the pmu_user.c file.
Finally, let's edit the makefile so it compiles the pmu_user kernel module:
obj-m := pmu_user.o
SRC := $(shell pwd)
all:
$(MAKE) -C $(KERNEL_SRC) M=$(SRC)
modules_install:
$(MAKE) -C $(KERNEL_SRC) M=$(SRC) modules_install
clean:
rm -f *.o *~ core .depend .*.cmd *.ko *.mod.c
rm -f Module.markers Module.symvers modules.order
rm -rf .tmp_versions Modules.symvers
After that, the pmu-mod_0.1.bb needs to be updated like this:
SUMMARY = "pmu-user-module"
DESCRIPTION = "Enables user mode access to PMU registers"
LICENSE = "CLOSED"
LIC_FILES_CHKSUM = ""
SRCBRANCH = "master"
inherit module
SRC_URI = "git://git@bitbucket.sw.nxp.com/mag/pmu-user-module.git;protocol=ssh;branch=${SRCBRANCH}"
SRCREV = "${AUTOREV}"
S = "${WORKDIR}/git"
# The inherit of module.bbclass will automatically name module packages with
# "kernel-module-" prefix as required by the oe-core build environment.
RPROVIDES_${PN} += "kernel-module-pmu-user"
NOTE: LIC_FILES_CHKSUM and LICENSE must be provided, but let's keep it simple here.
Now it's time to add the created layer to the image. Let's move to the build directory:
#Go to your build directory
cd <imx-yocto-bsp>/<build dir>
#Add layer to bblayers.conf
bitbake-layers add-layer ../layers/meta-pmu/
One last step: add the recipe at the end of the local.conf file:
vi conf/local.conf#Add this line at the end of local.conf
IMAGE_INSTALL_append = " pmu-mod"
Now we can generate the image:
bitbake <name of image>
Note: This is only a brief document that explains how to incorporate an out-of-tree kernel module to the yocto image. However, it would be best to put the meta-pmu directory inside the sources/ directory and follow Yocto's best practices.
Once the image is ready and flashed to the board, we should be able to find the kernel module inside of /lib/modules/<your-release-version>/extra :
cd /lib/modules/5.10.52-lts-5.10.y+ga11753a89ec6/extra
We can load the kernel module using modprobe:
modprobe pmu_user
To check that it is currently loaded, we use lsmode:
lsmode