i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
The i.MX8QuadMax SMARC System On Module integrates Dual Cortex A72 + Quad Cortex A53 Cores, Dual GPU systems, 4K H.265 capable VPU dual failover-ready display controller based i.MX8 QuadMax SoC with on SOM Dual 10/100/1000 Mbps Ethernet PHY, USB 3.0 hub and IEEE 802.11a/b/g/n/ac Wi-Fi & Bluetooth 5.0 module.
View full article
The D-PHY PLL (in the red circle in the picture below) is the PLL that drives the MIPI Clock lane. It must be set in accordance with the video to be sent to the display.   Calculating the video bandwidth The video bandwidth is calculated with the following equation: Pixels per second = Horizontal res. x Vertical res. x Frame rate x Bits per pixel Taking as example the 1080p60 OLED display RM67191: Pixels per second = 1920 x 1080 x 60 x 24 Pixels per second = 2985984000 = 2,98Gpixels/sec Pixel clock calculation The Display pixel clock can be obtained on the display driver. In this example for RM67191, the pixel clock is 132Mpixel/sec, see file: panel-raydium-rm67191.c\panel\drm\gpu\drivers - linux-imx - i.MX Linux kernel  Line 530: .pixelclock = { 66000000, 132000000, 132000000 }, Or the number can be obtained with the following equation: pixel clock = (hactive + hfront_porch + hsync_len + hback_porch) x (vactive + vfront_porch + vsync_len + vback_porch) x frame rate pixel clock = (1080 + 20 + 2 +34) × (1920 + 10 + 2 + 4) x 60 pixel clock = 132000000 (rounded up) Bit clock calculation (clock lane) The mipi-dphy bit_clk is the output clock and is calculated on file sec-dsim.c (line 1283): sec-dsim.c\bridge\drm\gpu\drivers - linux-imx - i.MX Linux kernel  Bit clock can be calculated with the following equation: bit_clk = Pixel clock * Bits per pixel / Number of lanes In the case of 1980p60 (Raydium display), It is:   bit_clk = pixel clock * bits per pixel / number of lanes bit_clk = 132000000 * 24 / 4 bit_clk = 792000000 Other important timing parameters like 'p', 'm', 's' are obtained on the table in the following header file: sec_mipi_dphy_ln14lpp.h\imx\drm\gpu\drivers - linux-imx - i.MX Linux kernel 
View full article
This doc show: on i.MX8QXP MEK board, configure ov5640 sensor(parallel interface) output 5MP(2592x1944) RAW(Bayer) data at 15fps, and Parallel Capture Subsystem and Image Sensor Interface capture RAW RGB data, and i.MX8QXP GPU debayer RAW data then display image. HW: i.MX8QXP MEK board, MEK base board (to place the parallel camera), ov5640 sensor. SW: Linux 4.14.98_2.0.0 BSP, and patches in this doc.   Configure at camera sensor side A Bayer filter is a color filter array (CFA) for arranging RGB color filters on a square grid of photosensors. The filter pattern is 50% green, 25% red and 25% blue, hence is also called BGGR, RGBG ,GRGB, or RGGB. The ov5640 has an image array capable of operating at up to 15 fps in 5 megapixel (2592x1944) resolution. OV5640 support output formats: RAW(Bayer), RGB565/555/444,CCIR656, YUV422/420, YCbCr422, and compression. To make ov5640 output 5MP RAW data at 15fps, check my kernel patch imx8-ov5640-raw-capture-driver-4.14.98_2.0.0.diff which apply on i.MX Linux 4.14.98_2.0.0 BSP kernel code. Parallel interface ov5640, use ov5640_raw_setting[] array of drivers/media/platform/imx8/ov5640_v3.c. This register setting is come from ov5640 software application note and data sheet. Configure at i.MX8QXP side The Parallel Capture Subsystem consists of the Parallel Capture Interface (BT 656) and associated peripherals. It interfaces to the Parallel CSI sensor. This allows for up to 24 RGB data bits in parallel or for RGB components on consecutive clocks (up to 10-bit color depth). The formats supported are RGB, RAW and YUV 422. Below is Parallel Capture Subsystem diagram: For RAW format data, CSI_CTRL_REG of Parallel Capture Subsystem need configured as my patch, otherwise found cannot get correct data.   The multiple input sources (MIPI CSI, Parallel Capture) captures the pixel data and feeds it to the ISI. The ISI is responsible for capturing and pre-processing the pixel data from multiple input sources and storing them into the memory. Below is ISI diagram: For RAW format data, it should be bypass any processing pipeline of ISI, just use ISI to save it to memory.   Capture test code To capture the RAW data and save it to file, check my patch imx8_ov5640_raw_captupre_test_4.14.98_2.0.0_ga.diff which apply on i.MX Linux 4.14.98_2.0.0 BSP unit test code. Note the usage is: ./imx8_cap.out -of -cam 1 -fr 15 -fmt BA81 -ow 2592 -oh 1944 -num 100   Display RAW data The RAW data cannot be displayed directly, debayer process is needed to get complete red, green, blue color for each pixel. The debayer process if run on CPU, will cost much CPU time. To save CPU time, debayer could done by GPU. The method is, captured RAW data upload to GPU as texture , then GPU will do the debayer, then full color of each pixel will be got, then display it. To upload RAW camera data to GPU with zero memory copy, i will use i.MX8QXP GPU extension GL_VIV_direct_texture. It create a texture with direct access support. API glTexDirectVIVMap,  which support mapping a user space memory or a physical address into the texture surface. The API glTexDirectVIVMap need logic and physical address of data buffer, so i will allocate data buffer from g2d lib, it is dma-buffer also get logic/physical address of buffer, then queue it as DMABUF to v4l2 capture driver, after dequeue got RAW camera data, pass it to GPU for debayer. GPU side, I will use OpenGL shader code from "Efficient, High-Quality Bayer Demosaic Filtering on GPUs". Check my patch imx8_debayer-gpusdk-5.3.0.diff which apply on i.MX GPU SDK 5.3.0 code. Note, here i only do is debayer, no extra process.   Known issue One thing is ov5640 output 5MP at 15fps, compare with output 5MP at 5fps, there are more noise of camera data at 15fps case. My debug found is, this noise seems come from ov5640 itself.   Reference: a>https://www.nxp.com/webapp/Download?colCode=IMX8DQXPRM b>https://www.nxp.com/webapp/Download?colCode=L4.14.98_2.0.0_MX8QXP&appType=license c>https://github.com/NXPmicro/gtec-demo-framework d>ov5640 data sheet e>ov5640 software application note f>Efficient, High-Quality Bayer Demosaic Filtering on GPUs https://www.semanticscholar.org/paper/Efficient%2C-High-Quality-Bayer-Demosaic-Filtering-on-McGuire/088a2f47b7ab99c78d41623bdfaf4acdb02358fb
View full article
This doc show: on i.MX6Q SabreSD board, configure ov5640 sensor(parallel or MIPI) output 5MP(2592x1944) RAW(Bayer) data at 15fps,and i.MX6Q IPU capture RAW RGB data, and i.MX6Q GPU debayer RAW data then display image. HW: i.MX6Q-SabreSD board, ov5640 sensor. SW: Linux 4.14.98_2.0.0 BSP, and patches in this doc. Configure at camera sensor side A Bayer filter is a color filter array (CFA) for arranging RGB color filters on a square grid of photosensors. The filter pattern is 50% green, 25% red and 25% blue, hence is also called BGGR, RGBG ,GRGB, or RGGB. The ov5640 has an image array capable of operating at up to 15 fps in 5 megapixel (2592x1944) resolution. OV5640 support output formats: RAW(Bayer), RGB565/555/444,CCIR656, YUV422/420, YCbCr422, and compression. To make ov5640 output 5MP RAW data at 15fps, check my patch imx6_ov5640_dvp_mipi_raw_capture_driver-4.14.98_2.0.0.diff which apply on i.MX Linux 4.14.98_2.0.0 BSP kernel code: Parallel interface ov5640, use ov5640_raw_setting[] array of drivers/media/platform/mxc/capture/ov5640.c. This register setting is come from ov5640 software application note and data sheet. MIPI interface ov5640, use ov5640_mipi_raw_setting[] array of drivers/media/platform/mxc/capture/ov5640_mipi.c. This register setting is combine setting of original code (remove ISP register setting), plus PLL register setting for MIPI interface, plus some data format register setting. Configure at i.MX6Q side The i.MX6Q IPU camera port(CSI-2 module) support data format include Raw(Bayer), RGB, YUV 4:4:4, YUV 4:2:2 and grayscale, up to 16 bits per value. Below is camera data routing for i.MX6Q:    Below is i.MX6Q IPU block daigram: The CSI-2 of IPU which is responsible for synchronizing and packing the video (or generic data) and sending it to other blocks. The video data received by CSI-2, could be sent to three other blocks: SMFC, VDI, IC. For RAW (Bayer) data capture, should go through path like this: CSI-2-->SMFC-->IDMAC-->DDR memory It means RAW data is received as generic data, see IPU_PIX_FMT_GENERIC in my patch, and IPU cannot process this kind data, it is just received to DDR memory. For MIPI interface camera, need note is i.MX6 side MIPI D-PHY clock must be calibrated to the actual clock range of the camera sensor’s D-PHY clock and the calibrated value must be equal to or greater than the camera sensor clock, detail see  AN5305. Take MIPI ov5640 as example: Pixel clock = 2592x1944x15fpsx(1/2 cycle/pixel)x1.35 blank interval = 51MHZ MIPI data rate = 51MHZ x 16 bit = 816Mb/s so 816/2/2*2 is 408MHZ is i.MX6 side D-PHY clock. Here due to one bayer pixel is 8bit, and i.MX6 MIPI data bus is 16 bit, so above use 1/2 cycle/pixel. And check ov5640_mipi_raw_setting[], you will got the sensor side D-PHY clock is about 672/2 = 336MHZ. And check AN5305, register MIPI_CSI2_PHY_TST_CTRL1 of i.MX6 need set as 0xC, but here i still keep it as default BSP value 0x14.   3.Capture test code I changed unit test mxc_v4l2_capture.c to capture the RAW data and save it to file. Check my patch imx6_ov5640_raw_captupre_test_4.14.98_2.0.0_ga.diff which apply on i.MX  Linux 4.14.98_2.0.0 BSP unit test code. Note the usage is: ./cap.out -c 1 -i 1 -fr 15 -m 6 -iw 2592 -ih 1944 -ow 2592 -oh 1944 -f BA81 -d /dev/video1 savefile.dmp parameter -i 1 means use CSI to MEM mode /dev/video1 is MIPI ov5640, /dev/video0 is parallel ov5640   4.Display RAW data The RAW data cannot be displayed directly, debayer process is needed to get complete red, green, blue color for each pixel. The debayer process if run on CPU, will cost much CPU time. To save CPU time, debayer could done by GPU. The method is, captured RAW data upload to GPU as texture , then GPU will do the debayer, then full color of each pixel will be got, then display it. To upload RAW camera data to GPU with zero memory copy, i will use i.MX6Q GPU extension GL_VIV_direct_texture. It create a texture with direct access support. API glTexDirectVIVMap,  which support mapping a user space memory or a physical address into the texture surface. The API glTexDirectVIVMap need logic and physical address of data buffer, so i will allocate data buffer from /dev/mxc_ipu, it is dma-buffer also get logic/physical address of buffer, then queue it as USERPTR to ipu v4l2 capture driver, after dequeue got RAW camera data, pass it to GPU for debayer. GPU side, I will use OpenGL shader code from "Efficient, High-Quality Bayer Demosaic Filtering on GPUs". Check my patch imx6-5640-debayer-testcode-gpusdk-5.2.0.diff which apply on i.MX GPU SDK 5.2.0 code. Note, here i only do is debayer, no extra process.   Known issue One thing is ov5640 output 5MP at 15fps, compare with output 5MP at 5fps, there are more noise of camera data at 15fps case. My debug found is , this noise seems come from ov5640 itself.   Reference: a>https://www.nxp.com/webapp/Download?colCode=IMX6DQRM b>https://www.nxp.com/webapp/Download?colCode=L4.14.98_2.0.0_MX6QDLSOLOX&appType=license c>https://github.com/NXPmicro/gtec-demo-framework d>https://www.nxp.com/docs/en/application-note/AN5305.pdf e>ov5640 data sheet f>ov5640 software application note g>Efficient, High-Quality Bayer Demosaic Filtering on GPUs https://www.semanticscholar.org/paper/Efficient%2C-High-Quality-Bayer-Demosaic-Filtering-on-McGuire/088a2f47b7ab99c78d41623bdfaf4acdb02358fb
View full article
In defaut Linux BSP, NXP implemented LVDS to HDMI(it6263) and MIPI-DSI to HDMI(adv7535) bridge chip drivers. And these drivers need read the EDID from display, then apply the timing parameters to DRM driver. But for the use case that bridge chip -> Serializer -> Deserializer -> LCD Panel use case, there is no EDID. The attached are reference patches for such use case, it combined the bridge chip to panel directly, and no EDID is needed. The patches are tested on iMX8QXP MEK with bridge chip + panel mode, both of them can see the fb0 device under /sys/class/graphics/ folder, also can see card under  /sys/class/drm/. Display works fine with DTS selected 720P panel mode. [2020-06-24]: Add patches for L4.14.98 kernel: Android_Auto_P9.0.0_GA2.1.0_Kernel_No_EDID_IT6263.patch L4.14.98-iMX8QXP-MEK-ADV7535-MIPI-DSI-to-HDMI-bridge-chip-com.patch
View full article
This document describes the i.MX 8QXP MEK mini-SAS connectors features on Linux and Android use cases, covering the supported daughter cards, the process to change Device Tree (DTS) files or Boot images, and enable these different display options on the board.
View full article
This document describes the i.MX 8MQ EVK HDMI output and mini-SAS connectors features on Linux and Android use cases, covering the supported daughter-board, the process to change Device Tree (DTS) files or Boot Images, and enable these different display options on the board.
View full article
Requirements: Host machine with Ubuntu 14.04 UDOO Quad/Dual Board uSD card with at least 8 GB Download documentation and install latest Official Udoobuntu OS (at the moment of writing: UDOObuntu 2.1.2), https://www.udoo.org/downloads/   Overview: This document describes how to install and test Keras (Open source neural network library) and Theano (numerical computation library for python ) for deep learning library usage on i.MX6QD UDOO board.  Installation: $ sudo apt-get update && sudo apt-get upgrade update your date system: e.g. $ sudo date -s “07/08/2017 12:00” First satisfy the run-time and build time dependencies: $ sudo apt-get install python-software-properties software-properties-common make unzip zlib1g-dev git pkg-config autoconf automake libtool curl  python-pip python-numpy libblas-dev liblapack-dev python-dev libatlas-base-dev gfortran libhdf5-serial-dev libhdf5-dev python-setuptools libyaml-dev libpython2.7-dev $ sudo easy_install scipy The last step is installing scipy through pip, and can take several hours. Theano First, we have a few more dependencies to get: $sudo pip install scikit-learn $sudo pip install pillow $sudo pip install h5py With these dependencies met, we can install a stable Theano release from the git source: $ git clone https://github.com/Theano/Theano $ cd Theano Numpy 1.9 cause conflicts with armv7, so we need to change the setup.py configuration: $ sudo nano setup.py Remove line    #       install_requires=['numpy>=1.9.1', 'scipy>=0.14', 'six>=1.9.0'], And add setup_requires=["numpy"], install_requires=["numpy"], Then install it: $ sudo python setup.py install Keras The installation can occur with the command: (this could take a lot of time!!!) $ cd .. $ git clone https://github.com/fchollet/keras.git $ cd keras $ sudo python setup.py install $ LC_ALL=C $sudo pip install --upgrade keras After Keras is installed, you will want to edit the Keras configuration file ~/.keras/keras.json to use Theano instead of the default TensorFlow backend. If it isn't there, you can create it. This requires changing two lines. The first change is: "image_dim_ordering": "tf"  --> "image_dim_ordering": "th" and the second: "backend": "tensorflow" --> "backend": "theano" (The final file should look like the example below) sudo nano ~/.keras/keras.json {     "image_dim_ordering": "th",     "epsilon": 1e-07,     "floatx": "float32",     "image_data_format": "channels_last",     "backend": "theano" } You can also define the environment variable KERAS_BACKEND and this will override what is defined in your config file : $ KERAS_BACKEND=theano python -c "from keras import backend" Testing Quick test: udooer@udoo:~$ python Python 2.7.6 (default, Oct 26 2016, 20:46:32) [GCC 4.8.4] on linux2 Type "help", "copyright", "credits" or "license" for more information. >>> import keras Using Theano backend. >>>  Test 2: Be aware this test take some time (~1hr on udoo dual): $ curl -sSL -k https://github.com/fchollet/keras/raw/master/examples/mnist_mlp.py | python Output: For demonstration, deep-learning-models repository provided by pyimagesearch and from fchollet git, and also have three Keras models (VGG16, VGG19, and ResNet50) online — these networks are pre-trained on the ImageNet dataset, meaning that they can recognize 1,000 common object classes out-of-the-box. $ cd keras $ git clone https://github.com/fchollet/deep-learning-models $ Cd deep-learning-models $ ls -l Notice how we have four Python files. The resnet50.py , vgg16.py , and vgg19.py  files correspond to their respective network architecture definitions. The imagenet_utils  file, as the name suggests, contains a couple helper functions that allow us to prepare images for classification as well as obtain the final class label predictions from the network Classify ImageNet classes with ResNet50 ResNet50 model, with weights pre-trained on ImageNet. This model is available for both the Theano and TensorFlow backend, and can be built both with "channels_first" data format (channels, height, width) or "channels_last" data format (height, width, channels). The default input size for this model is 224x224. We are now ready to write some Python code to classify image contents utilizing  convolutional Neural Networks (CNNs) pre-trained on the ImageNet dataset. For udoo Quad/Dual use ResNet50 due to avoid space conflict. Also we are going to use ImageNet (http://image-net.org/) that is an image database organized according to the WordNet hierarchy, in which each node of the hierarchy is depicted by hundreds and thousands of images. from keras.applications.resnet50 import ResNet50 from keras.preprocessing import image from keras.applications.resnet50 import preprocess_input, decode_predictions import numpy as np   model = ResNet50(weights='imagenet')   #for this sample I download the image from: http://i.imgur.com/wpxMwsR.jpg  img_path = 'elephant.jpg' img = image.load_img(img_path, target_size=(224, 224)) x = image.img_to_array(img) x = np.expand_dims(x, axis=0) x = preprocess_input(x)   preds = model.predict(x) # decode the results into a list of tuples (class, description, probability) # (one such list for each sample in the batch) print('Predicted:', decode_predictions(preds, top=3)[0]) Save the file an run it. Results for elephant image: Top prediction was 0.8890 for African Elephant Testing with this image: http://i.imgur.com/4FIOwAN.jpg Results: Top prediction was: 0.7799 for golden_retriever. Now your Udoo is ready to use Keras and Theano as Deep Learning libraries, next time we are going to show some usage example for image classification models with OpenCV. References: GitHub - fchollet/keras: Deep Learning library for Python. Runs on TensorFlow, Theano, or CNTK.  GitHub - Theano/Theano: Theano is a Python library that allows you to define, optimize, and evaluate mathematical expres…  GitHub - fchollet/deep-learning-models: Keras code and weights files for popular deep learning models.  Installing Keras for deep learning - PyImageSearch 
View full article
Overview As more and more communication required between online and offline, the QR code is widely used in the mobile payment, mobile small apps, industry things identification and etc. The i.MX6UL/ULL has the IP of CSI and PXP for camera connection and image CSC/FLIP/ROTATION acceleration. A LCDIF IP is supporting the display, but no 3D IP support. This means this low power and low end AP is very suitable for the industry HMI segment, which does not require a cool 3D graphic display, but a simple and straightforward GUI for interaction. QR code scanner is one of the use cases in the industry segment, which more and more customer are focusing on. The i.MX6UL CPU freq of i.MX6UL is about 500Mhz, and it does not have GPU IP, so a lightweight GUI and window system is required. Here we recommend the QT with wayland backend (without X11), which would make the window system small and faster than traditional X11 UI. Why chose QT is because of it has open source version, rich components, platform independent, good performance for embedded system and strong development staffs like QtCreator for creating application. How to enable the QT development environment, check this: Enable QT developement for i.MX6UL (v2)  Here I made a QR code scanner demo based on QT5.6 + QZXing (QR/Bar code scan engine) running on the i.MX6UL EVK board with a UVC camera (at least 640x480 resolution is required) and 480x272px LCD. Source code is open here (License Apache2.0): https://github.com/muddog/QRScanner  Implementation To do camera preview and capture, you must think on the gstreamer first, which is easy use and has the acceleration pads which implemented by NXP for i.MX6UL. Yes, it's very easy for you to enable the preview in console like: $ gst-launch-1.0 v4l2src device=/dev/video1 ! video/x-raw,format=YUY2,width=640,height=320 ! imxvideoconvert_pxp ! video/x-raw,format=RGB16 ! waylandsink It works under the i.MX6UL EVK, with PXP IP to do color space convert from YUY2 -> RGB16 acceleration, also the potential scaling of the image. The CPU loading of this is about 20-30%, but if you use the component of "videoconvert" to replace the "imxvideoconvert_pxp", we do CSC and scale by CPU, then the loading would increase to 50-60%. The "/dev/video1" is the device node for UVC camera, it may different in your environment. So our target is clear, create such pipeline (with PXP acceleration) in the QT application, and use a appsink to get preview images, do simple "sink" to one QWidget by drawing this image on the widget surface for preview (say every 50ms for 20fps). Then in other thread, we fetch the preview buffer in a fixed frequency (like every 0.5s), then feed it into the ZXing engine to decode the strings inside this image. Here are the class created inside the source code: ScannerQWidgetSink It act as a gstreamer sink for preview rendering. Init the pipeline, create a timer with timeout every 50ms. In the timer handler, we use appsink to copy the camera buffer from gstreamer, and tell the ViewfinderWidget to do update (re-draw event). ViewfinderWidget This class inherit from the QWidget, which draw the preview buffer as a QImage onto it's own surface by using QPainter. The QImage is created at the very begining with the image buffer created by the ScannerQWidgetSink. Because QImage itself does not maintain the image buffer, so the buffer must be alive during it's usage. So we keep this buffer during the ScannerQWidgetSink life cycle, copy the appsink buffer from pipeline to it for preview. MainWindow Create main window, which does not have title bar and border. Start any animation for the red line scan bar. Create instance of DecoderThread and ScannerQWidgetSink. Setup and start them. DecoderThread A infinite loop, to wait for a available buffer released by the ScannerQWidgetSink every 0.5s. Copy the buffer data to it's own buffer (imgData) to avoid any change to the buffer by sink when doing decoding. Then feed this copy of buffer into ZXing engine to get decoder result. Then show on the QLabel. Screenshot under wayland (weston) desktop: Customize Camera instance Now I use the UVC camera which pluged in the USB host, which device node is /dev/video1. If you want to use CSI or other device, please change the construction parameters for ScannerQWidgetSink(): sink = new ScannerQWidgetSink(ui->widget, QString("v4l2src device=/dev/video1")); Image resolution captured and review Change the static member value of ScannerQWidgetSink class: uint ScannerQWidgetSink::CAPTURE_HEIGHT = 480; uint ScannerQWidgetSink::CAPTURE_WIDTH = 640; Preview fps and decoding frequency Find the "framerate=20/1" strings in the ScannerQWidgetSink::GstPipelineInit(), change to your fps. You also have to change the renderTimer start timeout value in the ::StartRender(). The decoding frequency is determined by renderCnt, which determine after how many preview frames showed to feed the decoder. Main window size It's fixed size of main window, you have to change the mainwindow.ui. It's easy to do in the QtCreate Designer. FAQ Why not use CSI camera in demo? Honestly, I do not have CSI camera module, it's also DNP when you buying the board on NXP.com. So a widely used UVC camera is preferred, it's also easy for you to scan QR code on your phone, your display panel etc. Why not use QCamera to do preview and capture? The QCamera class in the Qtmultimedia component uses the camerabin2 gstreamer plugin, which create a very long pipeline for different usage of viewfinder, image capture and video encoder. Camerabin2 would eat too much CPU and memory resource, take picture and recording are very very slow. The preview of 30fps would eat about 70-80% CPU loading even I hacked it using imxvideoconvert_pxp instread of software videoconvert. Finally I give up to implement the QRScanner based on QCamera. How to make sure only one instance of QT app is running? We can use QSharedMemory to create a share memory with a unique KEY. When second instance of app is started, it would check if the share memory with this KEY is created or not. If the shm is there, it means there's already one instance running, it has to exit(). But as the QT mentioned, the QSharedMemory can not be destroyed correctly when app crashed, this means we have to handle each terminate signal, and do delete by ourselves: static QSharedMemory *gShm = NULL; static void terminate(int signum) {    if (gShm) {       delete gShm;       gShm = NULL;    }    qDebug() << "Terminate with signal:" << signum;    exit(128 + signum); } int main(int argc, char *argv[]) {    QApplication a(argc, argv);    // Handle any further termination signals to ensure the    // QSharedMemory block is deleted even if the process crashes    signal(SIGHUP, terminate ); // 1    signal(SIGINT, terminate ); // 2    signal(SIGQUIT, terminate ); // 3    signal(SIGILL, terminate ); // 4    signal(SIGABRT, terminate ); // 6    signal(SIGFPE, terminate ); // 8    signal(SIGBUS, terminate ); // 10    signal(SIGSEGV, terminate ); // 11    signal(SIGSYS, terminate ); // 12    signal(SIGPIPE, terminate ); // 13    signal(SIGALRM, terminate ); // 14    signal(SIGTERM, terminate ); // 15    signal(SIGXCPU, terminate ); // 24    signal(SIGXFSZ, terminate ); // 25    gShm = new QSharedMemory("QRScannerNXP");    if (!gShm->create(4, QSharedMemory::ReadWrite)) {       delete gShm;       qDebug() << "Only allow one instance of QRScanner";       exit(0);    } .....
View full article
When configuring i.MX6 IPU IDMAC CPMEM parameters or debugging it, it's hard to find the value of a parameter inside the 160 bits word. This web tool separates the 160 bits words into parameters making it easier to check their values. Link: i.MX Tools 
View full article
Two IPUs are supported in i.MX6Q SoC, each IPU supports 1920x1080 resolution, and 4 kinds of interfaces on i.MX6Q PADs can be used to connect display devices: HDMI, Digital RGB24, LVDS1+LVDS2, MIPI DSI. In the documents, we will discuss how to expand VGA port with digital RGB and realize dual-display via HDMI & VGA, The solution has been validated on Android4.2.2 and Android4.4.2 BSP released by NXP. 1.  Expanding VGA port based on digital RGB24 interface with ADV7125 Schematic is in attachments. 2. Configurations of envionment variables in u-boot The following settings are for booting via NFS, users can adjust them to boot via Flash on board. setenv ipaddr 192.168.1.103 setenv serverip 192.168.1.102 setenv gateway 192.168.1.1 setenv ethaddr 00:04:9f:00:ea:d3 setenv bootargs_base 'setenv bootargs console=ttymxc0,115200' setenv bootargs_android 'setenv bootargs ${bootargs} init=/init androidboot.console=ttymxc0 androidboot.hardware=freescale' setenv bootargs_nfs 'setenv bootargs ${bootargs} ip=${ipaddr}:${serverip}:${gateway}:${netmask}::eth0 off root=/dev/nfs nfsroot=${serverip}:${nfsroot}' setenv bootargs_disp 'setenv bootargs ${bootargs} video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32 video=mxcfb1:dev=lcd,1920x1080M@60,if=RGB24,bpp=32 video=mxcfb2:off fbmem=32M vmalloc=400M' setenv bootcmd_net 'run bootargs_base bootargs_android bootargs_nfs bootargs_disp;tftpboot ${loadaddr} uImage;bootm' 3. Configurations in BSP file (1)IOMUX of DISP0 port (in header file)     MX6Q_PAD_DI0_DISP_CLK__IPU1_DI0_DISP_CLK,     MX6Q_PAD_DI0_PIN15__IPU1_DI0_PIN15,        /* DE */     MX6Q_PAD_DI0_PIN2__IPU1_DI0_PIN2,        /* HSync */     MX6Q_PAD_DI0_PIN3__IPU1_DI0_PIN3,        /* VSync */     MX6Q_PAD_DISP0_DAT0__IPU1_DISP0_DAT_0,     MX6Q_PAD_DISP0_DAT1__IPU1_DISP0_DAT_1,     MX6Q_PAD_DISP0_DAT2__IPU1_DISP0_DAT_2,     MX6Q_PAD_DISP0_DAT3__IPU1_DISP0_DAT_3,     MX6Q_PAD_DISP0_DAT4__IPU1_DISP0_DAT_4,     MX6Q_PAD_DISP0_DAT5__IPU1_DISP0_DAT_5,     MX6Q_PAD_DISP0_DAT6__IPU1_DISP0_DAT_6,     MX6Q_PAD_DISP0_DAT7__IPU1_DISP0_DAT_7,     MX6Q_PAD_DISP0_DAT8__IPU1_DISP0_DAT_8,     MX6Q_PAD_DISP0_DAT9__IPU1_DISP0_DAT_9,     MX6Q_PAD_DISP0_DAT10__IPU1_DISP0_DAT_10,     MX6Q_PAD_DISP0_DAT11__IPU1_DISP0_DAT_11,     MX6Q_PAD_DISP0_DAT12__IPU1_DISP0_DAT_12,     MX6Q_PAD_DISP0_DAT13__IPU1_DISP0_DAT_13,     MX6Q_PAD_DISP0_DAT14__IPU1_DISP0_DAT_14,     MX6Q_PAD_DISP0_DAT15__IPU1_DISP0_DAT_15,     MX6Q_PAD_DISP0_DAT16__IPU1_DISP0_DAT_16,     MX6Q_PAD_DISP0_DAT17__IPU1_DISP0_DAT_17,     MX6Q_PAD_DISP0_DAT18__IPU1_DISP0_DAT_18,     MX6Q_PAD_DISP0_DAT19__IPU1_DISP0_DAT_19,     MX6Q_PAD_DISP0_DAT20__IPU1_DISP0_DAT_20,     MX6Q_PAD_DISP0_DAT21__IPU1_DISP0_DAT_21,     MX6Q_PAD_DISP0_DAT22__IPU1_DISP0_DAT_22,     MX6Q_PAD_DISP0_DAT23__IPU1_DISP0_DAT_23,     MX6Q_PAD_NANDF_D4__GPIO_2_4,        /* ADV7125 Power on / off (2) Frame buffer static struct ipuv3_fb_platform_data qcorein_fb_data[] = { /*    {     .disp_dev = "ldb",     .interface_pix_fmt = IPU_PIX_FMT_RGB666,     .mode_str = "LDB-WXGA",     .default_bpp = 16,     .int_clk = false,     .late_init = false,     }, */     {     .disp_dev = "hdmi",     .interface_pix_fmt = IPU_PIX_FMT_RGB24,     .mode_str = "1920x1080M@60",     .default_bpp = 32,     .int_clk = false,     .late_init = false,     },     {     .disp_dev = "lcd",     .interface_pix_fmt = IPU_PIX_FMT_RGB24,     .mode_str = "1920x1080",     .default_bpp = 32,     .int_clk = false,     }, }; (3) Settings about IPUs /* HDMI -- IPU1_DI0 */ static struct fsl_mxc_hdmi_core_platform_data hdmi_core_data = {     .ipu_id = 1,     .disp_id = 1, }; /* RGB24 DISP0 LCD(Here is RGB24-->VGA via ADV7125 -- IPU0_DI0 */ static struct fsl_mxc_lcd_platform_data lcdif_data = {     .ipu_id = 0,     .disp_id = 0,     .default_ifmt = IPU_PIX_FMT_RGB24, }; (4) Adding LCD data in board_init() funtion static void __init mx6_qcorein_board_init(void) { .... imx6q_add_lcdif(&lcdif_data); ... } (5) Adding mxc_lcd.c driver to linux kernel When using make menuconfig to configure kernel, don't forget to add LCD driver to kernel.  Note: If users are using other version of android BSP, she can do porting according to above thinking. Weidong Sun NXP TIC team
View full article
MIPI can support video streaming over 1, 2, 3 and 4 lanes. On i.MX6 Sabre boards, the OV5640 camera supports 1 or 2 lanes and the NXP Linux Kernel uses 2 lanes as default. In order to use only one lane, follow the steps below: 1 - Change the board Device Tree on Linux Kernel. On file <linux kernel folder>/arch/arm/boot/dts/imx6qdl-sabresd.dtsi, find the entry "&mipi_csi" and change lanes from 2 to 1. 2 - Configure OV5640 to use only one lane instead of two. On file <linux kernel folder>/drivers/media/platform/mxc/capture/ov5640_mipi.c, change the register 0x300e value from 0x45 to 0x05. This register setup is located at struct ov5640_init_setting_30fps_VGA. 3 - Build the kernel and device tree files. 4 - Test the camera. Unit test can be used to test the video capture: /unit_tests/mxc_v4l2_overlay.out -di /dev/video1 -ow 1024 -oh 768 -m 1 5 - Checking if it's really using one lane. MIPI_CSI_PHY_STATE resgister (address 0x021D_C014) provides the status of all data and clock lanes. During video streaming using 2 lanes, the register value constantly changes its value between 0x0000_0300 and 0x0000_0330. When using only one lane, this register value constantly changes its value between 0x0000_0300 and 0x0000_0310. To read the register value during the stream, run the video test with &: /unit_tests/mxc_v4l2_overlay.out -di /dev/video1 -ow 1024 -oh 768 -m 1 & Now, run the memtool: /unit_tests/memtool -32 0x021dc014 1 i.MX6DL running mxc_v4l2_overlay.out with only one lane:
View full article
Hardware connection: there are two board-to-board connectors on E-INK daughter card IMXEBOOKDC4, while there is only one on i.MX7D Sabre board, as the picture below. This might be a bit confusing to connect the two: Checked with internal, the original design was trying to wire both eLCDIF and EPDC bus out to one daughter card, add the flexibility to have different configurations on one display daughter card(LCD/EPD). On i.MX7D Sabre board, only one connector is available for EPDC bus. Here is how we connect i.MX7D Sabre and IMXEBOOKDC4: Software setup: here we use pre-build L3.14.38_6UL7D_Beta Linux as our boot-image, steps to setup/boot/test EPDC: 1. download and decompress BSP pre-build image package "L3.14.38_beta_images_MX6UL7D.tar.gz", you should be able to find the SD image in it -- "fsl-image-gui-x11-imx7dsabresd.sdcard" 2. program the SD image on your SD card(>800 MBytes) with command(I'm running this in Ubuntu): "dd if=fsl-image-gui-x11-imx7dsabresd.sdcard of=/dev/sdb;sync" 3. insert SD card to the slot(J6) on i.MX7D Sabre board, connect debug-UART and power-on the board 4. modify the u-boot environment variables as below:      a.) setenv fdt_file imx7d-sdb-epdc.dtb           (originally this is "fdt_file=imx7d-sdb.dtb")      b.) setenv mmcargs 'setenv bootargs console=${console},${baudrate} root=${mmcroot} epdc video=mxcepdcfb:E060SCM,bpp=16'           (originally this is "mmcargs=setenv bootargs console=${console},${baudrate} root=${mmcroot}") 5. boot into Linux kernel, run unit-test: "/unit_tests/mxc_epdc_fb_test.out", should be able to have test patterns running on EPD.
View full article
Display on LVDS0 or LVDS1 is normal, but some customer need  larger screen and they need the dual LVDS work on the same time. In another word, it is to use the dual 8 connection. Here I give the simple introduction on this. Environment Board: MCIMX6Q-SDP (Or the board customer design) BSP:  Linux or Android BSP provided by Freescale Screen: M190PW01-V8 19(Take this as example) Steps: 1\ Hardware connection Make sure the hardware connection is right. The 4 pairs of difference signals on both LVDS0 and LVDS1 work, but in our reference board MCIMX6Q-SDP only 3 pairs of difference signals work. To make this screen working well the connection must be proper connect. Take the screen M190PW01-V8 19 as a example, the connection is as follow: 2\ Software modify Here we can know the screen works on the RGB24 mode not the RGB666, as the connection is already right. So the next step is to modify the code. As customers use differently screens, they have to porting the screen driver first.  About porting customers need to modify the  ldb.c  according to the datasheet of the screen in BSP. The parameters and timing should be set right.  Also the board.c need to be modified, RGB24 mode should also be set. About the porting Lvds screen steps, details you can refer to the Porting LVDS LCD With Low Resolution to i.MX6  in our community. 3\ Command special in u-boot After porting success the LVDS  and build the BSP. The run the images built on the board then boot up the board. In the u-boot the command should be set, about the display section is : video=mxcfb0:dev=ldb,LDB-1080P60,if=RGB24 ldb=spl0. The default BSP provided by Freescale is support dual LVDS display, but the display mode should be right so it can work well. Hope this can give some help to you.
View full article
The attached is the document and sample code for iMX5 system 80 interface LCD driver based on IPUV3. It is based on iMX51 2.6.31_09.12 BSP (SDK 1.7), tested on iMX53 3-Stack board. 1. Description This is Smartlcd driver for Freescale MX51 SDK1.7 release. (Kernel: 2.6.31_09.12.00/01)  2. File List -- Smartlcd_giantplus_4_IMX51_Linux_2.6.31_09.12.01.patch: SmartLCD panel support patch, and unit test code. -- Sample.config: the config file for reference. -- readme.txt: this file, please refer to it before use the package. -- SmartLCD Structure.pptx: the basic structure for smartlcd on IPUv3. 3. Requirement - MX51_3DS Green board(TO2.0) - No hardware rework needed, only need plug the giantplus GMA722A0 to J10. - MX51 SDK1.7 release package - L2.6.31_09.12.00_SDK_source.tar.gz                                - redboot_200952.zip 4. How to use 4.1 How to use demo -- Program default redboot.bin to board via ATKtools -- Copy attached zImage to tftp folder (assume /tftpboot) -- extract default rootfs to NFS folder (assume /nfsroot) -- COPY attached imx51_fb_test to ~/unit_test folder. -- Power on the board -- After redboot is boot up, use following command to boot up linux kernel    load -r -b 0x100000 zImage    exec -c "noinitrd console=ttymxc0 root=/dev/nfsroot rootfstype=nfsroot nfsroot=10.192.225.221:/nfsroot/rootfs rw ip=dhcp" -- Once the linux kernel launched, run following commands to test smartlcd panel.    cd /unit_tests    ./imx51_fb_test 4.2 How to use source code -- Current release code is based on L2.6.31_09.12.00_SDK_source.tar.gz. Extract the file to your working folder. -- Entering the working folder and type "./install", select a folder to install ltib. (such as .../ltib) -- Entering ltib folder and type "./ltib" to build Linux platform.  If you are not familiar with this setp, please refer to doc "i.MX_3Stack_SDK_UserGuide.pdf" for detail. -- Entering folder ".../ltib/rpm/BUILD/linux", copy "Smartlcd_giantplus_4_IMX51_Linux_2.6.31_09.12.01.patch" from release package to current folder    Run command "patch -p1 < Smartlcd_giantplus_4_IMX51_Linux_2.6.31_09.12.01.patch" -- When complete, run command "make ARCH=arm menuconfig", and you can refer to attached sample.config for detail.    * enable    Device Drivers ----> Graphics support ----> [*]   Asynchronous Panels                                            ----> [*] GiantPlus 240x320 Panel                                             * disable    Device Drivers ----> Graphics support ----> [ ]   Synchronous Panel Framebuffer                                         ----> Multimedia support    ----> [ ]   Video For Linux                                             -- Run command "make ARCH=arm" to build kernel.  4.3 How to do SMARTLCD driver test -- After Smartlcd_giantplus_4_IMX51_Linux_2.6.31_09.12.01.patch applied, there will be an folder "IMX51_TEST" under linux. -- Go to that folder, and run "make ARCH=arm", imx51_fb_test will be created. -- Copy imx51_fb_test to rootfs/unit_test. and run. 5. History N/A 6. Known Issue -- V4L2 not working yet.
View full article
It is based on L3.0.35_GA4.1.0 BSP.   In default Linux BSP, there are 3 kinds of de-interlace mode, motion =0,1,2 mode, motion mode 0 and 1 will use three fields for de-interlace, and motion mode 2 wil use one field for de-interlace, so the whole fps is 30. In this mode, for motion mode 0 and 1, field 1,2,3 was used for first VDI output frame of display; and field 3,4,5 was used for second VDI output frame of display; field 5,6,7 was used for third VDI output frame of display. One field data (such as 2,4,6) was used only once, so there is data lost.   After applied these patches, the VDI de-interlace output will be 60fps: for motion mode 0 and 1, field 0,1,2 was used for first VDI output frame of display; and field 1,2,3 was used for second VDI output frame of display; field 2,3,4 was used for third VDI output frame of display. So all field data will be used twice, there is no video data lost, the VDI quality was improved.   Kernel patches: 0001-Add-MEM-to-VDI-to-MEM-support-for-IPU.patch 0002-Add-IPU-IC-memcpy-support.patch 0003-IPU-VDI-support-switch-odd-and-even-field-in-motion-.patch 0004-IPU-VDI-correct-vdi-top-field-setting.patch   mxc_v4l2_tvin_imx6_vdi_60fps.zip: this is the test application sample code.   Test commands, parameter "-vd" means double fps VDI: ./mxc_v4l2_tvin.out -ol 0 -ot 0 -ow 720 -oh 480 -m 0 -vd  
View full article
For iMX6DQ, there are two IPUs, so they can support up to 4 cameras at the same time. But the default BSP can only support up to two cameras at the same time.     The attached patch can make the BSP support up to 4 cameras based on 3.10.53 GA 1.1.0 BSP.   The 4 cameras can be: - 1xCSI, 3xMIPI - 2xCSI, 2xMIPI - 4xMIPI   For 4xMIPI case, the four cameras should be combined on the single MIPI CSI2 interface, and each camera data should be transfered on a mipi virtual channel.   In this patch, we given the example driver for Intersil ISL79985. The input to ISL79985 is four CVBS camera. There are four patches: 0001-IPU-update-IPU-capture-driver-to-support-up-to-four-.patch      Updated IPU common code to support up to four cameras.   0002-Add-Intersil-ISL79985-MIPI-Video-Decoder-Driver-for-.patch      ISL79985 driver, which can support both 1 lanes and 2 lanes mode.   0003-Remove-the-page-size-align-requirement-for-v4l2-capt.patch      With this patch, the mxc_v4l2_tvin test application can use overlay framebuffer as V4l2 capture buffer directly.   0004-IPU-CSI-Drop-1-2-frame-on-MIPI-interface-for-interla.patch      This patch is option, it will drop one field data, so for each camera, the input will be 720*240 30 FPS.   For 720P HD solution, it is based on Maxim MAX9286: iMX6DQ MAX9286 MIPI CSI2 720P camera surround view solution for Linux BSP   How to builld the kernel with ISL79985 support:       make imx_v7_defconfig       make menuconfig (In this command, you should select the ISL79985 driver:             Device Drivers  --->                   <*> Multimedia support  --->                         [*]   V4L platform devices  --->                               <*>   MXC Video For Linux Video Capture                                       MXC Camera/V4L2 PRP Features support  --->                                           <*>Intersil ISL79985 Video Decoder support                                           <*>mxc VADC support                                           <*>Select Overlay Rounting (Queue ipu device for overlay library)                                           <*>Pre-processor Encoder library                                           <*>IPU CSI Encoder library)       make zImage       make dtbs   The built out image file:       arch/arm/boot/dts/imx6q-sabresd.dtb       arch/arm/boot/zImage   "mxc_v4l2_tvin.zip" is the test application, test command to capture the four cameras and render on 1080P HDMI display: /mxc_v4l2_tvin.out -ol 0 -ot 0 -ow 960 -oh 540 -d 1 -x 0 -g2d & /mxc_v4l2_tvin.out -ol 960 -ot 0 -ow 960 -oh 540 -d 1 -x 1 -g2d & /mxc_v4l2_tvin.out -ol 0 -ot 540 -ow 960 -oh 540 -d 1 -x 2 -g2d & /mxc_v4l2_tvin.out -ol 960 -ot 540 -ow 960 -oh 540 -d 1 -x 3 -g2d &   2015-10-10 Update: Updated the test application "mxc_v4l2_tvin_isl79985.tar.gz" to fix the Yocto build errors. Updated ISL79985 register setting "page5, isl79985_write_reg(0x07, 0x46)" in patch "0002-Add-Intersil-ISL79985-MIPI-Video-Decoder-Driver-for-.patch", which can fix the green line issue.   2016-01-25 Update: Added de-interlace support, L3.10.53_ISL79985_Surroundview_Patch_20160125.tar.gz New test capplication for de-interlance: mxc_v4l2_tvin_isl79985_vdi_20160125.tar.gz New test commands: /mxc_v4l2_tvin.out -ol 0 -ot 0 -ow 960 -oh 540 -d 1 -x 0 -g2d -m & /mxc_v4l2_tvin.out -ol 960 -ot 0 -ow 960 -oh 540 -d 1 -x 1 -g2d -m & /mxc_v4l2_tvin.out -ol 0 -ot 540 -ow 960 -oh 540 -d 1 -x 2 -g2d -m & /mxc_v4l2_tvin.out -ol 960 -ot 540 -ow 960 -oh 540 -d 1 -x 3 -g2d -m &   Note:  with the 0005-Add-interlaced-mode-capture-for-ISL79985.patch, the V4l2 capture driver will return 720x480 video size, but only odd lines have the video data, they are filled in line skip line mode.     2016-11-21 Update: Added ISL79987 support, L3.10.53_ISL7998x_Surroundview_Patch_20161121.zip New test capplication for de-interlance support: mxc_v4l2_tvin_isl7998x.tar.gz   Test commands (without de-interlace): /mxc_v4l2_tvin.out -ol 0 -ot 0 -ow 960 -oh 540 -d 1 -x 0 -g2d & /mxc_v4l2_tvin.out -ol 960 -ot 0 -ow 960 -oh 540 -d 1 -x 1 -g2d & /mxc_v4l2_tvin.out -ol 0 -ot 540 -ow 960 -oh 540 -d 1 -x 2 -g2d & /mxc_v4l2_tvin.out -ol 960 -ot 540 -ow 960 -oh 540 -d 1 -x 3 -g2d &   Test commands (with de-interlace, for ISL79987 only): /mxc_v4l2_tvin.out -ol 0 -ot 0 -ow 960 -oh 540 -d 1 -x 0 -m 1 -g2d & /mxc_v4l2_tvin.out -ol 960 -ot 0 -ow 960 -oh 540 -d 1 -x 1 -m 1 -g2d & /mxc_v4l2_tvin.out -ol 0 -ot 540 -ow 960 -oh 540 -d 1 -x 2 -m 1 -g2d & /mxc_v4l2_tvin.out -ol 960 -ot 540 -ow 960 -oh 540 -d 1 -x 3 -m 1 -g2d &     Now the same patch can support both ISL79985 and ISL79987, with NTSC CVBS camera, for ISL79985, it captures 60fps 720*240; for ISL79987, it captures 30fps 720*480.   2016-11-22 Update: Added patch for L4.1.15 BSP, it supports both ISL79985 and ISL79987, L4.1.15_ISL7998x_Surroundview_Patch_20161122.zip Test capplication mxc_v4l2_tvin_isl7998x.tar.gz is re-used.
View full article
By default Linux BSP will work with LVDS screen on i.MX 6SoloX SABRE board. To enable MCIMX28LCD on the board, following need to be modified in u-boot: setenv panel 'MCIMX28LCD' setenv fdt_file 'imx6sx-sdb-lcdif1.dtb' #add video=mxc_lcdif:SEIKO-WVGA,bpp=16 to kernel command line you’re using #For example, when booting from MMC it will be: #  setenv mmcargs 'setenv bootargs console=${console},${baudrate} root=${mmcroot} video=mxc_lcdif:SEIKO-WVGA,bpp=16' saveenv
View full article
                                                                                         Watch the Freescale i.MX team boot up Android 5.0 Lollipop in i.mx6 application processors—在线播放—优酷网,视频高清在线观看 The Freescale i.MX Android team has booted up Android 5.0 Lollipop in the SABRE platform for i.mx6 series. Google pushed all of the latest source for its Android release to AOSP on Nov. 5, and the Freescale Android Team started their work. With the previous 6 days to boot Android Lollipop up, the Freescale i.MX Android team enabled the basic features like connectivity, audio/video playback, sensors, inputs and display on day 7! You can see the some changes in the demo video at the beginning of the post. The Freescale i.MX Android team has closely followed almost every version of Android since it is released by AOSP and has good experience on it. Below are some snapshots and pictures for the Android Lollipop.
View full article
It is based on 3.0.35 GA 4.1.0 BSP.   0001-Correct-mipi-camera-virtual-channel-setting-in-ipu_c.patch It is the updated IPU code for MIPI ID and SMFC setting in ipu_capture.c. These setting should not be combined with MIPI virtual channel value, they shoule be fixed with ID 0.   0002-Use-virtual-channel-3-for-ov5640-mipi-camera-on-iMX6.patch The sample code to modify ov5640_mipi camera to use virtual channel 3 on SabreSD board.   The followed command can be used to verify the mipi camera function after booted into Linux: $ gst-launch mfw_v4lsrc capture-mode=1 device=/dev/video1 ! mfw_v4lsink     2014-09-30 update: Added the patch for 3.10.17_GA1.0.0 BSP. "L3.10.17_1.0.0_mipi_camera_virtual_channel_3.zip"  
View full article