i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
  Introduction   Prior to 6.1.22_2.0.0 BSP release, Bluetooth interface are based on the tty line discipline framework, so we need to use hciattach tool to enable it in the user space. From 6.1.22_2.0.0 BSP, the nxp bluetooth driver no longer needs the help of the userspace hciattach tool, and the tty port bound by bluetooth also won't be exported to the user space, so you cannot find the corresponding tty device anymore. So, you won't see the (/dev/ttymxcX), for the Bluetooth interface. All jobs has been done in the new NXP Bluetooth driver. New Method   The new NXP Bluetooth UART Driver is based on a server driver for the NXP BT serial protocol, which can enable the built-in Bluetooth device inside an NXP BT chip. This driver has a Power Save feature that will put the chip into a sleep state whenever there is no activity for 2000ms and will be woken up when any activity is to be initiated over UART.  Device Tree support The new BT framework requires adding a "bluetooth" sub node with a device compatibility string to the attached UART node in the dts file &uart1 { bluetooth { compatibility = "nxp,88w8987-bt"; fw-init-baudrate = <3000000>; #Optional. Default is considered 115200 if this parameter not defined. }; };   Note: The parameter ‘compatibility = “nxp,88w8987-bt”’ will use for 88W8987, IW416, 88Q9098, IW612 chipsets and need to change for 88W8997 with parameter ‘compatibility = “nxp,88w8997-bt”’.   Note: ’fw-init-baudrate’ parameter depends on the module vendor. The Murata and Azuere wifi modules support in BSP release uses the default value -- 115200. We strongly recommend looking at the module vendor-specific baud rate parameter. Note: For the old 88Q9098 Murata 1XL module that uses the 3Mbps by default, please add the fw-init-baudrate = <3000000> property in dts files to make it work. Enable Guide   Use wifi interface to load combo (wifi & bt) firmware and enable BT Need to load wifi driver first, then load the BT driver, otherwise, BT driver suspend/resume test will fail. This is a HW limitation, since NXP wifi and BT module use the same power control pin(W_DISABLE1#), if we don't load the wifi driver, SDIO bus will power down the wifi chip during suspend resume, which may cause the BT chip also been powered down and cannot work after resume back. So we need to load the wifi driver to make sure SDIO bus won't power down the BT chip to make sure BT functions can work during suspend resume. modprobe moal mod_para=nxp/wifi_mod_para.conf modprobe btnxpuart or insmod mlan.ko insmod moal.ko mod_para=nxp/wifi_mod_para.conf insmod btnxpuart   Unload UART Driver modprobe moal Make sure run hciconfig hci0 up or hciconfig hci0 reset or bluetootctl power on before unload btnxpuart driver. If we don't open hci0 interface, the driver cannot send change to 115200 baud rate command to BT chip, which causes the host and BT chip baud rate mismatch, the host still uses 115200bps talk to the BT chip which now use 3Mbps, it cannot work anymore. So we need to make sure open the hci0 interface before unload btnxpuart driver.   mod_para=nxp/wifi_mod_para.conf modprobe btnxpuart sleep 3 hciconfig hci0 up #Note: Need to up hci interface before unload the BT module hcitool -i hci0 cmd 3F 23 02 00 00 modprobe -r btnxpuart modprobe -r moal sleep 3​ For better reference: Please find the I.MX 8MQ Linux getting started user guide, UM11483, Chapter "7.1 Bring-up using NXP Bluetooth UART driver"  Bluetooth Deep Sleep Feature App Note AN13920, Chapter 6 Load NXP UART driver module NOTE: Please do not run the power save feature for Murata IW612 2EL Module Regards, Mario
View full article
In the i.MX8MP support 3 SDIO interface, and in the reference board i.MX 8M Plus LPDDR4 EVK design default use the eMMC connect to the USDHC3 to boot up from emmc,use the SD card connect to the USDHC2 port. When the U-Boot starts, it will detect the starting slot and automatically set mmcdev and mmcroot, for the USDHC3 in the default Linux set is mmc dev 2. But some customer need to change to the mmc dev 0, make the mmc0 work, see the following introduction.   1 For the EMMC         MMC (multiMedia card) is a communication protocol that supports two modes, SPI and MMC. EMMC is a chip that supports MMC protocol. Both eMMC and SD card package the flash controller and NAND Flash together, but their interfaces are different. eMMC is generally BGA packaged and soldered on PCB.   EMMC includes 11 signals, namely CLK, CMD, DATA0-7 and Data Strobe. The specific signals are as follows: CLK: It is used to output clock signal from the host side, synchronize data transmission and drive device operation. Each cycle can be transmitted on the rising or falling edge, or both CMD: The signal is mainly used by the host to send a command to the eMMC and the eMMC to send a response to the host. DAT0-7: DAT0-7 signal is mainly used for data transmission between Host and eMMC. After the eMMC is powered on or soft reset, only DAT0 can transmit data. After initialization, DAT0-3 or DAT0-7 can be configured for data transmission, that is, the data bus can be configured as 4 bits or 8 bits. Data Strobe: The clock signal is sent to the host by eMMC with the same frequency as the CLK signal. It is used for synchronization of data reception at the host side. The Data Strobe signal can only be configured and enabled in the HS400 mode. After being enabled, the stability of data transmission can be improved and the bus tuning process can be omitted. 2 For the EMMC design on the i.MX8MP LPDDR4 EVK 2.1 The i.MX8MP The i.MX8MP there is 3 SDIO interface,and the i.MX8MP has 3 USDHC ports:USDHC1, USDHC2 and USDHC3.   At i MX8MP supports SD/MMC/eSD/eMMC/SDXC, and starts and boots using the USDHC port based on setting of the BOOT_MODE[3:0] pins.       In the reference design, eMMC is connected to USDHC3, and SD card is connected to USDHC2. USDHC3 is used as the eMMC boot device by default on the development board. We can see the detailed definitions of the three USDHC interfaces in the reference manual. Among them, USDHC1 and USDHC3 are 8 bits and support 8-bit data, while USDHC2 only supports 4-bit data.   2.2 Hardware and software design   The hardware design is as shown above. The eMMC is connected to the SD3 interface, and the software is configured in this way by default. 2.3 The port number of the default BSP In the i.MX 8M Plus LPDDR4 EVK development board design, the eMMC is connected to the USDHC3 as the default boot device When the U-Boot starts, it will detect the starting slot, and automatically set mmcdev and mmcroot. For USDHC3, the default is mmc dev 2.   The device structure of SD/MMC cards is similar. MMC should be the predecessor of SD, but the design of MMC at that time was half that of SD. Therefore, the SD/MMC driver is universal, and the device node of Linux continues the name of MMC.   Meaning of blk: blk is a block device, and the number after ⾯ is the serial number of the device   Meaning of p: p indicates partition, and p1 is the first partition   We can see the correspondence between the USDHC interface and the mmc under Linux. The kernel MMC module now uses a fixed mmcblk index for the uSDHC slot. The default BSP is "mmc2=&usdhc3":   In the design of the MX 8M Plus LPDDR4 EVK development board, by default, the eMMC is connected to the USDHC3, SD3 is used, and mmcblk2 is used in the SD3 slot. When setting the kernel parameters in the u-boot, you can see that: ### select mmc dev 2 (USDHC3) on the i.MX 8M Mini EVK, i.MX 8M Nano EVK, and i.MX 8M Plus EVK: U-Boot > mmc dev 2 0 For the emmc the related port is :mmcblk2 By default, the flash target is MMC: 2 after the Demo images burning of the development board is started.   3 mmc0 work as emmc device and boot up We need to modify the device, u-boot, kernel related part for the mmc0 work on the android BSP, 3.1 Software modify 2.2.1 u-boot: Dts section root/arch/arm/dts/imx8mp-evk.dts: memory@40000000 {                  device_type = "memory";                  reg = <0x0 0x40000000 0 0xc0000000>,                        <0x1 0x00000000 0 0xc0000000>;         }; aliases { /* SD/MMC: eMMC/SD slot numbering fix */        mmc0 = &usdhc3; /*Modify the usdhc3 and mmc0, default is mmc2*/        mmc1 = &usdhc2; /* usdhc2 and mmc0 do not change*/        mmc2 = &usdhc1; /*Modify the usdhc1 to mmc2, make the usdhc1 work*/         }; reg_can1_stby: regulator-can1-stby {…..} Board secton: root/board/freescale/imx8mp_evk/imx8mp_evk.c int board_init(void) {         struct arm_smccc_res res; } int board_mmc_get_env_dev(int devno) {        if(devno == 0)         return devno + 2;           else if (devno == 2)         return devno - 2;           else         return devno; }   int mmc_map_to_kernel_blk(int devno) {         return devno; } int board_late_init(void) {         board_late_mmc_env_init(); } SPL: root/common/spl/spl_mmc.c int spl_mmc_load_image(struct spl_image_info *spl_image,                         struct spl_boot_device *bootdev) {…..} Default settings:     2.2.2 kernel section: In the kernel section need to change all the related mmcblk2 to mmcblk0.                   2.2.3 device section modify: Change all the related mmcblk2 to mmcblk0. Change the uuu_imx_android_flash.bat /android_build/device/nxp/common/tools/fastboot_imx_flashall.bat if not [%soc_name:imx8mp=%] == [%soc_name%] (  set vid=0x1fc9& set pid=00x0146& set chip=MX8MP  set uboot_env_start=0x2000& set uboot_env_len=0x8  - set emmc_num=2& set sd_num=1 + set emmc_num=0& set sd_num=1  set board=evk  goto :device_info_end   All the modify see the Patch in the attachment.
View full article
In some cases, such as mass production or preparing a demo. We need u-boot environment stored in demo sdcard mirror image.  Here is a way: HW:  i.MX8MP evk SW:  LF_v5.15.52-2.1.0_images_IMX8MPEVK.zip The idea is to use fw_setenv to set the sdcard mirror as the operation on a real emmc/sdcard. Add test=ABCD in u-boot-initial-env for test purpose. And use fw_printenv to check and use hexdump to double confirm it. The uboot env is already written into sdcard mirror(imx-image-multimedia-imx8mpevk.wic). All those operations are on the host x86/x64 PC. ./fw_setenv -c fw_env.config -f u-boot-initial-env Environment WRONG, copy 0 Cannot read environment, using default ./fw_printenv -c fw_env.config Environment OK, copy 0 jh_root_dtb=imx8mp-evk-root.dtb loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${bsp_script}; mmc_boot=if mmc dev ${devnum}; then devtype=mmc; run scan_dev_for_boot_part; fi arch=arm baudrate=115200 ...... ...... ...... splashimage=0x50000000 test=ABCD usb_boot=usb start; if usb dev ${devnum}; then devtype=usb; run scan_dev_for_boot_part; fi vendor=freescale hexdump -s 0x400000 -n 2000 -C imx-image-multimedia-imx8mpevk.wic 00400000 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 |................| hexdump -s 0x400000 -n 10000 -C imx-image-multimedia-imx8mpevk.wic 00400000 5f a4 9b 97 20 6a 68 5f 72 6f 6f 74 5f 64 74 62 |_... jh_root_dtb| 00400010 3d 69 6d 78 38 6d 70 2d 65 76 6b 2d 72 6f 6f 74 |=imx8mp-evk-root| 00400020 2e 64 74 62 00 20 6c 6f 61 64 62 6f 6f 74 73 63 |.dtb. loadbootsc| 00400030 72 69 70 74 3d 66 61 74 6c 6f 61 64 20 6d 6d 63 |ript=fatload mmc| 00400040 20 24 7b 6d 6d 63 64 65 76 7d 3a 24 7b 6d 6d 63 | ${mmcdev}:${mmc| 00400050 70 61 72 74 7d 20 24 7b 6c 6f 61 64 61 64 64 72 |part} ${loadaddr| 00400060 7d 20 24 7b 62 73 70 5f 73 63 72 69 70 74 7d 3b |} ${bsp_script};| 00400070 00 20 6d 6d 63 5f 62 6f 6f 74 3d 69 66 20 6d 6d |. mmc_boot=if mm| ...... ...... ...... 00401390 76 3d 31 00 73 6f 63 3d 69 6d 78 38 6d 00 73 70 |v=1.soc=imx8m.sp| 004013a0 6c 61 73 68 69 6d 61 67 65 3d 30 78 35 30 30 30 |lashimage=0x5000| 004013b0 30 30 30 30 00 74 65 73 74 3d 41 42 43 44 00 75 |0000.test=ABCD.u| 004013c0 73 62 5f 62 6f 6f 74 3d 75 73 62 20 73 74 61 72 |sb_boot=usb star| 004013d0 74 3b 20 69 66 20 75 73 62 20 64 65 76 20 24 7b |t; if usb dev ${| 004013e0 64 65 76 6e 75 6d 7d 3b 20 74 68 65 6e 20 64 65 |devnum}; then de| flash the sdcard mirror into i.MX8MP evk board emmc to check uuu -b emmc_all imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk imx-image-multimedia-imx8mpevk.wic  The first time boot, the enviroment is already there.  How to achieve that: a. fw_setenv/fw_printenv: https://github.com/sbabic/libubootenv.git Note: Please do not use uboot fw_setenv/fw_printenv Compile it on the host x86/x64 PC. It is used on host. b. u-boot-initial-env Under uboot, make u-boot-initial-env Note: Yocto deploys u-boot-initial-env by default c. fw_env.config  imx-image-multimedia-imx8mpevk.wic 0x400000 0x4000 0x400000 0x4000 are from uboot-imx\configs\imx8mp_evk_defconfig CONFIG_ENV_SIZE=0x4000 CONFIG_ENV_OFFSET=0x400000 Now, you can run  ./fw_setenv -c fw_env.config -f u-boot-initial-env
View full article
Introduction ARM SoC+FPGA/CPLD is widely used in some application like industry control and data acquisition system, there were many customers adopted i.MX6 EIM (a memory parallel interface) to access FPGA/CPLD, and archived good data throughput, but EIM is removed from i.MX8M and i.MX9, some customers is asking for such a compatible solution for i.MX8/8M and coming i.MX9 family.  FlexSPI is designed for connecting storage devices like NOR Flash, integrated in most of i.MXRT/i.MX8/LS products and provides flexible configuration for 4-wire/8wire working mode, this article provides a low-cost and efficiency demo to show how  to support CPLD/FPGA  via FlexSPI, as a replacement of EIM for EP i.MX8/9/LS products. key features Implement a  new kernel driver for FlexSPI to support read/write access to FPGA/CPLD. Support two type connections: Support 4-wire(QSPI) and 8-wire(HypeBUS, OctalSPI) Deliverables A new kernel driver for FlexSPI to support read/write access to FPGA/CPLD by AHB command A kernel patch to disable the QSPI Flash in kernel A test program shows how to do read/write performance test. Hardware Hardware Prepare: i.MX8MM-LPDDR4-EVK Lattice LFE5U EVK Figure1 4-wire SPI HW Block diagram Figure2 8-wire OctalSPI   Hardware Rework on i.MX8MM-EVK     1 Need to remove the SPI-Flash(U5, MT25QU256ABA) on the i.MX8MM-EVK board, and wire below signals: QSPI_DATA0 QSPI_DATA1 QSPI_DATA2 QSPI_DATA3 QSPI_SCLK QSPI_nSS0 VDD_1V8 GND Figure3 QPSI signals for FPGA/CPLD Figure4 Hardware rework on i.MX8MM-EVK board Note that, i.MX8MM-EVK QSPI power rails is 1.8v, so be careful that the FPGA/CPLD side IO should be 1.8V. Software BSP version 1 Linux BSP version: L5.10.52 Software Change  Apply 0001-FlexSPI-FPGA-need-to-disable-flexspi-for-fpga-usage.patch in Linux kernel and generate the new dtb extract the flexspi-fpga driver compile the flexspi-fpga driver with the kernel$ $make -C $(YOUR_KDIR) M=$(FlexSPI_FPGAW_DIVER_DIR) modules ARCH=arm64 CROSS_COMPILE=$(CROSS_COMPILE) Deployment  upload new generated i.mx8mm-evk.dtb to the target board(the 1st partition) upload the flex-spi driver and fpga/cpld test program to the target board   Test Test1: Set the flexspi working at 40Mhz   $insmod imx_flexspi_fpga.ko pre_div=2 post_div=5 Read/write FPGA/CPLD test .$/flexspi_fpga_test -p 0x08000000 -s 768 Test2: Set the FlexSPI working at 100MHz   $ insmod imx_flexspi_fpga.ko pre_div=1 post_div=4 Read/write FPGA/CPLD test $./flexspi_fpga_test -p 0x08000000 -s 768   Limitation FPGA and Flash devices can’t work at the same time due to just one FlexSPI controller. Due to the IO assignment conflict in i.MX8M EVK design, this demo just tested 4-wire(QSPI) mode at 50MHz and got data throughput as expected. Disclaimer: − “Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.”
View full article
Environment BSP: L6.1.22_2.0.0​ Platform: i.MX93 Links:  https://github.com/NXP/swupdate-scripts https://github.com/nxp-imx-support/meta-swupdate-imx   The AN13872 provides us the swupdate yocto layer, swupdate-scripts and test steps, but there is still much to add. The purpose of this knowledge base is to provide customized advice. 1.How to port meta-swupdate-imx to any yocto version you want? As meta-swupdate-imx only provide kirkstone version, we can upgrade or degrade it based on this version. We will take L6.1.22_2.0.0​ porting steps as an example. 1.1 Download Yocto layer  cd imx-yocto-bsp/sources git clone https://github.com/sbabic/meta-swupdate.git -b mickledore git clone https://github.com/nxp-imx-support/meta-swupdate-imx.git 1.2 Modify  Yocto layer  imx-yocto-bsp/sources/meta-swupdate-imx/conf/layer.conf   You can find swupdate version in imx-yocto-bsp/sources/meta-swupdate/recipes-support/swupdate/ 1.3 Handle patches in meta-swupdate-imx/recipes-bsp/u-boot/files/ About patchs in sources/meta-swupdate-imx/recipes-bsp/u-boot/files/ and imx-yocto-bsp/sources/meta-swupdate-imx/recipes-support/swupdate/files/, you need use devtool to unpack uboot and swupdate into workspace and add changes manunally for development. CONFIG_ENV_OFFSET_REDUND=CONFIG_ENV_OFFSET+CONFIG_ENV_SIZE   sources/meta-swupdate-imx/recipes-bsp/u-boot/u-boot-imx_%.bbappend 2.How to flash base image? Use uuu or dd command, just like common imx-image-xxx 3.swupdate-scripts porting suggestions 3.1 Partition table You can modify partition table refer the size of images. For different soc, the first offset is different. If you are porting i.MX8MP based on iMX8MM, the offset should be 32K.   3.2 Some errors 3.2.1 This error indicates that you need enlarge size of rootfs. e2fsck 1.45.5 (07-Jan-2020) The filesystem size (according to the superblock) is 887599 blocks The physical size of the device is 768000 blocks Either the superblock or the partition table is likely to be corrupt! Abort<y>?    3.2.2 You need upgrade e2fsck verison. e2fsck 1.46.5 (30-Dec-2021) /home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/slota/core-image-base-imx93-11x11-lpddr4x- evk.ext4 has unsupported feature(s): FEATURE_C12 e2fsck: Get a newer version of e2fsck! /home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/slota/core-image-base-imx93-11x11-lpddr4x- evk.ext4: ********** WARNING: Filesystem still has errors ********** resize2fs 1.46.5 (30-Dec-2021) resize2fs: Filesystem has unsupported feature(s) (/home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_ass  solution: wget https://mirrors.edge.kernel.org/pub/linux/kernel/people/tytso/e2fsprogs/v1.47.0/e2fsprogs-1.47.0.tar.xz tar -xf e2fsprogs-1.47.0.tar.xz cd e2fsprogs-1.47.0/ ./configure make -j16 sudo make install   3.2.3 mtools /home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/../utils/utils.sh: line 58: mdir: command not found /home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/../utils/utils.sh: line 66: mcopy: command not found /home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/../utils/utils.sh: line 66: mcopy: command not found /home/nxf65025/imx-yocto-bsp/swupdate-scripts/base_image_assembling/../utils/utils.sh: line 68: mdir: command not found solution: sudo apt-get install mtools
View full article
  Solution           
View full article
Hello everyone, this document will share an step by step guide of the configuration needed in a Linux PC to compile the SDK examples we provide, as well as how to download them in an easy way. Requirements: I.MX 8M Mini EVK SDK package (for i.MX8MM) UUU tool First step would be to get the SDK package, this include documentation and code, which is available at the MCUXpresso builder webpage: https://mcuxpresso.nxp.com/en/welcome Click on the select a development board and select the package for your development kit or the i.MX MPU   This guide is focused on Linux build so will select GCC package and Linux host PC as the environment. Click on build and wait for the SDK package to be ready for download. Note1: Click on select all if the whole middleware package is desired Note2: it is possible to select each middleware that are desired. On new window select download SDK Select on new pop-up window download both SDK and documentation Read and accept EULA so the download start Decompress the package using the following command: $ tar -xvzf ~/SDK_2_13_0_EVK-MIMX8MM.tar.gz -C ~/SDK_2_13_0_EVK-MIMX8MM Next will be to download the GCC from the ARM webpage, gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2 https://developer.arm.com/downloads/-/gnu-rm Note that the GCC version used is based on the minimum version required, since this was tested and supported, this could be found within the SDK documentation (~/SDK_2_13_0_EVK-MIMX8MM/docs/MCUXpresso SDK Release Notes for EVK-MIMX8MM) Once downloaded we can decompress and configure the environment: $ tar -xf gcc-arm-none-eabi-10.3-2021.10-x86_64-linux.tar.bz2 $ export ARMGCC_DIR=~/gcc-arm-none-eabi-10.3-2021.10 $ export PATH=$PATH:~/gcc-arm-none-eabi-10.3-2021.10 $ sudo apt-get install cmake  Check the version >= 3.0.x $ cmake --version Once this is done we enter the path of the example of our choice and compile using the script, as necessary using debug, release or all. $ cd ~/SDK_2_13_0_EVK-MIMX8MM/boards/evkmimx8mm/demo_apps/hello_world/armgcc $./build_release.sh The binary (elf and bin) will be found inside the folder according to whether we use debug or release script. For this example we used release script: $ cd release Once builded we can move/download the binaries from the Linux host PC to the board by using the UUU tool with the command fat_write #### we put the board in fastboot mode by entering the command in the uboot terminal fastboot 0 #### From the Linux terminal introduce the UUU command to  download to the FAT partition of the eMMC of the baord: ## For rproc it is needed the .elf binary ## $ uuu -v -b fat_write hello_world.elf mmc 0:1 hello_world.elf ## For bootaux it is needed the .bin binary ## $  uuu -v -b fat_write hello_world.bin mmc 0:1 hello_world.bin Once with the binaries in the FAT partition of the SD/eMMC of our board we can make the necessary modifications (device tree/bootargs) to test the Cortex-M examples. For any question regarding this document, please create a community thread and tag me if needed. Saludos/Regards, Aldo.
View full article
  Platform: i.MX8MP EVK , L6.1.22-2.0.0 LT9211 is a chip that can realize the conversion of MIPI DSI signals to LVDS signals. This patch is based on this mainline driver:https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/drivers/gpu/drm/bridge/lontium-lt9211.c Keypoint Move lt9211_host_attach function to lt9211_attach to skip bridge attach error.  
View full article
1.Compile full aosp or only kernel Build full aosp: source build/envsetup.sh lunch evk_8mm-userdebug ./imx-make.sh -j8  Only build kernel: ./imx-make.sh kernel -j8 2.Build GKI locally Download GKI outside of android_build. mkdir gki && cd gki (Make sure folder gki is not inside of ${MY_ANDROID}) repo init -u https://android.googlesource.com/kernel/manifest -b commonandroid13-5.15 repo sync Build GKI locally. BUILD_CONFIG=common/build.config.gki.aarch64 build/build.sh 3. Export symbols After building GKI locally, you can copy linux-imx from /vendor/nxp-opensource/kernel_imx into common. cd common rm -r ./* cp ${MY_ANDROID}/vendor/nxp-opensource/kernel_imx/* ./ ln -s ${MY_ANDROID}/vendor/nxp-opensource/verisilicon_sw_isp_vvcam verisilicon_sw_isp_vvcam ln -s ${MY_ANDROID}/vendor/nxp-opensource/nxp-mwifiex nxp-mwifiex  Build GKI about i.MX: BUILD_FOR_GKI=yes BUILD_CONFIG=common/build.config.imx EXT_MODULES_MAKEFILE="verisilicon_sw_isp_vvcam/vvcam/v4l2/Kbuild" EXT_MODULES="nxp-mwifiex/mxm_wifiex/wlan_src" build/build_abi.sh --update-symbol-list -j8 Then the  common/android/abi_gki_aarch64_imx will be generated. cd gki cp common/android/abi_gki_aarch64_imx /tmp/abi_gki_aarch64_imx   Update GKI kernel rm -r common/* # delete imx kernel repo sync # recover aosp kernel cp /tmp/abi_gki_aarch64_imx android/abi_gki_aarch64_imx cd .. BUILD_CONFIG=common/build.config.gki.aarch64 build/build_abi.sh LTO=thin --update -j8  Then, common/android/abi_gki_aarch64.xml is updated.  
View full article
Installing the new release (Ubuntu 22.04) was detected some NXP boards as iMX8MNEVK, iMX8MM-EVK, iMX8MP-EVK and iMX8ULP-EVK had an issue with the WIFI module that basically it does not initialize at boot. Remember, the supported WIFI modules in Ubuntu 22.04 in the EVKs are the following:       • NXP 88W8987       • NXP 88W9098       • NXP 88W8997       • NXP IW416       • NXP 88W8801       • NXP IW612 To initialize the WIFI module of NXP EVKs in Ubuntu 22.04 you can set the following command in console:   sudo modprobe moal mod_para=nxp/wifi_mod_para.conf   That command find the correct driver for our WIFI module and then initialize it, but this only works when Ubuntu is working and if you reset the EVK you need to set the command again.   The definitive solution is create a custom startup script as a service:   Step 1: Go to etc/systemd/system   cd etc/systemd/system   Step 2: In this directory create a new file with the name of your preference but the extension must be .service. You can do it with nano or vim: sudo nano or sudo vim   The file must contain: [Unit] Description=”Wifi Start” [Service] ExecStart=sudo modprobe moal mod_para=nxp/wifi_mod_para.conf [Install] WantedBy=multi-user.target   Now save the file, in my case the name was wifi_start.service.   Step 3: Now we need to enable the script in the startup/boot sequence following the command: sudo systemctl enable wifi_start.service   Remember in wifi_start.service is the name as you saved your file.   Finally, each time you boot your board, the WIFI module will initialize automatically.   Boards tested: iMX8MN (With WIFI module NXP 88W8987) iMX8MM (With WIFI module NXP 88W8987) iMX8MP (With WIFI module NXP 88W8997) iMX8ULP (With WIFI module NXP IW416)  
View full article
This demo for all(bootloader, device tree, Linux kernel, rootfs) in spi. It uses raw read(sf read)/raw write(sf write in uuu script) to achieve that. sf probe 0; sf read ${fdt_addr} 0x500000 0x100000; sf read ${loadaddr} 0x600000 0x1E00000; sf read ${initrd_addr} 0x2400000 0x600000; setenv bootargs console=${console},${baudrate} earlycon=${earlycon},${baudrate} rdinit=/linuxrc; booti ${loadaddr} ${initrd_addr} ${fdt_addr} |-- 0001-all-in-spi-demo-lf-5.10.72-2.2.0.patch --- patch for this demo |-- demo_binary | |-- flash.b0.bin --- b0 bootloader | |-- flash.bin --- c0 bootloader | |-- Image-imx8qxpc0mek.bin --- Linux kernel | |-- imx8qxp-mek.dtb --- device tree | |-- uramdisk_boot.rootfs.aarch64.img --- ram disk | |-- uuu.qspi.all.b0.uuu --- uuu script for b0 | `-- uuu.qspi.all.uuu --- uuu script for c0 `-- readme.txt --- this file # The spi layout used is: # - --------- -------------------------------------------- # | | flash.bin | env | dtb | Image |rootfs| # - --------------- -------------------------------------- # ^ ^ ^ ^ ^ ^ ^ # | | | | | | | # 0 4kiB 4MiB 5MiB 6MiB 36MiB 42MiB 0x1000 0x400000 0x500000 0x600000 0x2400000 Test: HW: i.MX8QXP MEK SW: lf-5.10.72-2.2.0 + 0001-all-in-spi-demo-lf-5.10.72-2.2.0.patch Test log: SF: Detected mt35xu512aba with page size 256 Bytes, erase size 128 KiB, total 64 MiB device 0 offset 0x500000, size 0x100000 SF: 1048576 bytes @ 0x500000 Read: OK device 0 offset 0x600000, size 0x1e00000 SF: 31457280 bytes @ 0x600000 Read: OK device 0 offset 0x2400000, size 0x600000 SF: 6291456 bytes @ 0x2400000 Read: OK [ 4.787552] imx6q-pcie 5f010000.pcie: unable to add pcie port. [ 4.797467] Freeing unused kernel memory: 2944K [ 4.807379] Run /linuxrc as init process Starting syslogd: OK Starting klogd: OK Running sysctl: OK Starting network: OK /bin/sh: can't access tty; job control turned off / #  
View full article
In this article, I will explain how to set up the iMX8M Plus to use the 4K Dart BCON Basler Camera module. Requirements: Evaluation Kit for the i.MX 8M Plus Applications Processor. (i.MX 8M Plus Evaluation Kit | NXP Semiconductors) Basler Camera for i.MX 8M Plus (4K dart BCON for MIPI camera module for i.MX 8M Plus | NXP Semiconductors). Embedded Linux for i.MX Applications Processors (Embedded Linux for i.MX Applications Processors | NXP Semiconductors) (For this example we will use BSP version Linux 5.15.71_2.2.0) Serial Console Emulator Basler Camera Specifications and Manuals: Basler Camera Specifications at this link: Embedded Vision Kits daA3840-30mc-IMX8MP-EVK - Embedded Vision Kits (baslerweb.com). Basler Manual to identify and setting up the hardware at this link: daA3840-30mc-IMX8MP-EVK | Basler Product Documentation (baslerweb.com) Basler Camera Module out-of-box with i.MX 8M Plus Applications Processor. (Video: Basler Camera Module out-of-box with i.MX 8M Plus Applications Processor | NXP Semiconductors) Steps After setting up the hardware we will need to turn on the iMX8M Plus and follow these steps: 1. Stop the boot process on Uboot by pressing any key. 2. Use the following command to list interfaces. => mmc list Output example => FSL_SDHC: 1 (SD) => FSL_SDHC: 2 The above command will show you the device number in this example for SD, the device number is 1. 3. Then use fatls <interface> <device[:partition]> [<directory>] fatls mmc 1:1 (Device 1 : Partition 1) With this command, we will be able to list device tree files. => fatls mmc 1:1 4. Select imx8mp-evk-basler.dtb or imx8mp-evk-dual-basler.dtb and use the command editenv fdtfile.  => editenv fdtfile Output example edit: imx8mp-evk-basler.dtb 5. In edit command line put the selected device tree (*.dtb). 6. Use saveenv command to save environment and continue with the boot process. 7. Using the terminal and go to /opt/imx8-isp/bin and execute the script run.sh. $ ./run.sh -c basler_1080p60 -lm 8. Use the command gst-device-monitor-1.0 to list devices. Here you will find the path to the camera device. $ gst-device-monitor-1.0 Output example Device found: name : VIV class : Video/Source caps : video/x-raw, format=YUY2, width=[ 176, 4096, 16 ], height=[ 144, 3072, 8 ], pixel-aspect-ratio=1/1, framerate={ (fraction)30/1, (fraction)29/1, (fraction)28/1, (fraction)27/1, (fraction)26/1, (fraction)25/1, (fraction)24/1, (fraction)23/1, (fraction)22/1, (fraction)21/1, (fraction)20/1, (fraction)19/1, (fraction)18/1, (fraction)17/1, (fraction)16/1, (fraction)15/1, (fraction)14/1, (fraction)13/1, (fraction)12/1, (fraction)11/1, (fraction)10/1, (fraction)9/1, (fraction)8/1, (fraction)7/1, (fraction)6/1, (fraction)5/1, (fraction)4/1, (fraction)3/1, (fraction)2/1, (fraction)1/1 } ... properties: udev-probed = true device.bus_path = platform-vvcam-video.0 sysfs.path = /sys/devices/platform/vvcam-video.0/video4linux/video2 device.subsystem = video4linux device.product.name = VIV device.capabilities = :capture: device.api = v4l2 device.path = /dev/video2 v4l2.device.driver = viv_v4l2_device v4l2.device.card = VIV v4l2.device.bus_info = platform:viv0 v4l2.device.version = 393473 (0x00060101) v4l2.device.capabilities = 2216693761 (0x84201001) v4l2.device.device_caps = 69206017 (0x04200001) gst-launch-1.0 v4l2src device=/dev/video2 ! ... 9. Finally, use gstreamer to verify proper operation. (With this gstreamer pipeline you will see a new window with the camera output. Then, just rotate the lens to acquire the correct focus) $ gst-launch-1.0 -v v4l2src device=/dev/video2 ! "video/x-raw,format=YUY2,width=1920,height=1080" ! queue ! imxvideoconvert_g2d ! waylandsink Basic description of Gstreamer Pipeline gst-launch-1.0 -v: The option -v enables the verbose mode to get detailed information of process. v4l2src device=/dev/video2: Select input device in this case the camera is on path /dev/video3. "video/x-raw,format=YUY2,width=1920,height=1080": Received format from camera. queue: This command is a buffer between camera recording process and the following image process, this command help us to interface two process and prevent blocking where each process has different speeds, in other words, when a process A is faster than process B. imxvideoconvert_g2d: This proprietary plugin uses hardware acceleration to perform rotation, scaling, and color space conversion on video frames. waylandsink : This command creates its own window and renders the decoded frames processed previously. 10. Result     I hope this article will be helpful. Best regards, Brian.
View full article
Hello everyone, We have recently migrated our Source code from CAF (Codeaurora) to Github, so i.MX NXP old recipes/manifest that point to Codeaurora eventually will be modified so it points correctly to Github to avoid any issues while fetching using Yocto. Also, all repo init commands for old releases should be changed from: $ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b <branch name> [ -m <release manifest>] To: $ repo init -u https://github.com/nxp-imx/imx-manifest -b <branch name> [ -m <release manifest>] This will also apply to all source code that was stored in Codeaurora, the new repository for all i.MX NXP source code is: https://github.com/nxp-imx For any issues regarding this, please create a community thread and/or a support ticket. Regards, Aldo.
View full article
Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the  i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response. i.MX 8M Family DDR Tools Overview The i.MX 8M Family DDR Tool is a Windows-based software to help users to do LPDDR4/DDR4/DDR3L training, stress test and DDR initial code generation for u-boot SPL. This page contains the latest releases for the i.MX 8M Family DDR Tools and cover the following SoCs : i.MX 8M Quad and its derivatives i.MX 8M Quadlite and i.MX 8M Dual i.MX 8M Mini Quad and its derivatives i.MX 8M Mini Quadlite/Dual/DualLite/Solo/SoloLite  i.MX 8M Nano Quad and its derivatives i.MX 8M Nano Quadlite/Dual/DualLite/Solo/SoloLite  i.MX 8M Plus   NOTE: For the i.MX 8/8X Family of DDR tools please refer to the: i.MX 8/8X Family DDR Tools Release   The purpose of the i.MX 8M Family DDR Tools is to enable users to generate and test a custom DRAM initialization based on their device configuration (density, number of chip selects, etc.) and board layout (data bus bit swizzling, etc.).  This process equips the user to then proceed with the bring-up of a boot loader and an OS.  Once the OS is brought up, it is recommended to run an OS-based memory test (like Linux memtester) to further verify and test the DDR memory interface.     The i.MX 8M Family DDR Tools consist of: DDR Register Programming Aid (RPA) MSCALE DDR Tool   For more details regarding these DDR tools and their usage, refer to the i.MX 8M DDR Tools User Guide.   i.MX 8M Family DDR Tool    The i.MX 8M Family DDR stress test tool is a Windows-based software tool that is used as a mechanism to verify that the DDR initialization is operational for use with u-boot and OS bring-up. To install the DDR Stress Test, save and extract the zip file mscale_ddr_tool_vXXX_setup.exe.zip   (where 'xxx' is the current version number) and follow the on-screen installation instructions.     i.MX 8M Family DDR Tool Requirements   The tool requires access to the Windows registry, hence users must run it in administrator mode. When users design new i.MX 8M Family boards, please make sure to follow the rules outlined in the respective Hardware Developers Guide and the MSCALE_DDR_Tool_User_Guide, which can help users bring up DDR devices on their respective i.MX 8M boards.   i.MX 8M Family DDR Tool User Guide   The i.MX 8M DDR tool includes the document: MSCALE_DDR_Tool_User_Guide NOTE: Please read the MSCALE_DDR_Tool_User_Guide inside the package carefully before you use this tool.   i.MX8M DDR Tool Revision History   Rev Major Changes* (Features) Comments 3.31 Integration of the workaround for 8MQ ERR051273   3.30 Fix DBI enabled issue for all i.MX 8M series Automatically identify ROHM and PCA9450 PMICs on i.MX 8M Nano board Fix 4GB/8GB memory tester issues   3.20 Add support to i.MX 8M Plus   3.10 Fixe UART communication issues for some specific characters between the PC software and the target board. Fine-tune DDRPHY registers in generated C code.   3.00 Add support to i.MX8M-nano Add support to different PMIC or PMIC configuration Add support to stress test for all DDR frequency points RPA tools for Nano include support for DDR3L, DDR4, and LPDDR4.   Note that the DDR3L and LPDDR4 RPAs contain the name preliminary only to denote that these RPAs are based on internal NXP validation boards where the DDR4 RPA is based on the released EVK.   2.10 Change DDR4 capacity computing method   2.00 Add support to i.MX8M-mini   * Further details available in the release notes   Sample configuration in the .ds script for i.MX 8M debug UART2: ################step 0: configure debug uart port. Assumes use of UART IO Pads.   ##### ##### If using non-UART pads (i.e. using other pads to mux out the UART signals), ##### ##### then it is up to the user to overwrite the following IO register settings   ##### memory set 0x3033023C 32 0x00000000 #IOMUXC_SW_MUX_UART2_RXD memory set 0x30330240 32 0x00000000 #IOMUXC_SW_MUX_UART2_TXD memory set 0x303304A4 32 0x0000000E #IOMUXC_SW_PAD_UART2_RXD memory set 0x303304A8 32 0x0000000E #IOMUXC_SW_PAD_UART2_TXD memory set 0x303304FC 32 0x00000000 #IOMUXC_SW_MUX_UART2_SEL_RXD sysparam set debug_uart   1 #UART index from 0 ('0' = UART1, '1' = UART2, '2' = UART3, '3' = UART4)   Sample configuration in the front of the .ds script for i.MX 8M debug UART3  ################step 0: configure debug uart port. Assumes use of UART IO Pads.   ##### ##### If using non-UART pads (i.e. using other pads to mux out the UART signals), ##### ##### then it is up to the user to overwrite the following IO register settings   ##### memory set 0x30330244 32 0x00000000 #IOMUXC_SW_MUX_UART3_RXD memory set 0x30330248 32 0x00000000 #IOMUXC_SW_MUX_UART3_TXD memory set 0x303304AC 32 0x0000000E #IOMUXC_SW_PAD_UART3_RXD memory set 0x303304B0 32 0x0000000E #IOMUXC_SW_PAD_UART3_TXD memory set 0x30330504 32 0x00000002 #IOMUXC_SW_MUX_UART3_SEL_RXD sysparam set debug_uart   2 #UART index from 0 ('0' = UART1, '1' = UART2, '2' = UART3, '3' = UART4)   Sample configuration in the front of the .ds script for i.MX 8M Mini PMIC configuration: ##############step 0.5: configure I2C port IO pads according to your PCB design.   ##### ########### You can modify the following instructions to adapt to your board PMIC ####### memory set 0x30330214 32 0x00000010  #IOMUXC_SW_MUX_I2C1_SCL memory set 0x30330218 32 0x00000010  #IOMUXC_SW_MUX_I2C1_SDA memory set 0x3033047C 32 0x000000C6 #IOMUXC_SW_PAD_I2C1_SCL memory set 0x30330480 32 0x000000C6  #IOMUXC_SW_PAD_I2C1_SDA sysparam set pmic_cfg 0x004B #bit[7:0] = PMIC addr,bit[15:8]=I2C Bus. Bus index from 0 ('0' = I2C1, '1' = I2C2, '2' = I2C3, '3' = I2C4) sysparam set pmic_set 0x2F01 #bit[7:0] = Reg val, bit[15:8]=Reg addr. #REG(0x2F) = 0x01 sysparam set pmic_set 0x0C02   #REG(0x0C) = 0x02 sysparam set pmic_set 0x171E   #REG(0x17) = 0x1E sysparam set pmic_set 0x0C00   #REG(0x0C) = 0x00 sysparam set pmic_set 0x2F11    #REG(0x2F)=0x11     i.MX 8M Family DDR Register Programming Aid (RPA) The i.MX 8M DDR RPA (or simply RPA) is an Excel spreadsheet tool used to develop DDR initialization for a user’s specific DDR configuration (DDR device type, density, etc.). The RPA generates the DDR initialization(in a separate Excel worksheet tab):   DDR Stress Test Script: This format is used specifically with the DDR stress test by first copying the contents in this worksheet tab and then pasting it to a text file, naming the document with the “.ds” file extension. The user will select this file when executing the DDR stress test. The How to Use Excel worksheet tab provides instructions on using the RPA   i.MX 8M Family DDR Register Programming Aid (RPA): Current Versions To obtain the latest RPAs, please refer to the following links (note, existing RPAs have been removed from this main page and moved to the SoC specific links below): i.MX 8M Quad : https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8M-m850D-DDR-Register-Programming-Aid-RPA/ta-p/1172441 i.MX 8M Mini : https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MMini-m845S-DDR-Register-Programming-Aid-RPA/ta-p/1172443 i.MX 8M Nano: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MNano-m815S-DDR-Register-Programming-Aid-RPA/ta-p/1172444 i.MX 8M Plus: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8MPlus-m865S-DDR-Register-Programming-Aids-RPA/ta-p/1235352   Processor Mask Revisions Memory Supported Latest RPA Version * i.MX 8M Quad & Derivatives All LPDDR4 Rev 33 i.MX 8M Quad & Derivatives All DDR4 Rev 18 i.MX 8M Quad & Derivatives All DDR3L Rev 9 i.MX 8M Mini & Derivatives A0 LPDDR4 Rev 22 i.MX 8M Mini & Derivatives A0 DDR4 Rev 21 i.MX 8M Mini & Derivatives A0 DDR3L Rev 10 i.MX 8M Nano & Derivatives A0 LPDDR4 Rev 9 i.MX 8M Nano & Derivatives A0 DDR4 Rev 12 i.MX 8M Nano & Derivatives A0 DDR3L Rev 6 i.MX 8M Plus & Derivatives A1 LPDDR4 Rev 9 i.MX 8M Plus & Derivatives A1 DDR4 Rev 9 * For the details about the updates, please refer to the Revision History tab of the respective RPA.    To modify the DRAM Frequency for a custom setting refer to iMX 8M Mini Register Programming Aid DRAM PLL setting    Related Resources Links: iMX 8M Mini Register Programming Aid DRAM PLL setting  i.MX 8/8X Series DDR Tool Release  i.MX 6/7 DDR Stress test GUI Tool i.MX 8M Application Processor Related Resources i.MX8M (m850D) DDR Register Programming Aid (RPA)  i.MX8MMini (m845S) DDR Register Programming Aid (RPA)  i.MX8MNano (m815S) DDR Register Programming Aid (RPA) i.MX 8MPlus (m865S) DDR Register Programming Aids (RPA)   i.MX 8ULP DDR tools: i.MX Software and Development Tools | NXP Semiconductors Scroll down to “Other Resources --> Tools --> DDR Tools”  
View full article
  This is a detailed programming aid for the registers associated with i.MX 8M Plus DDR initialization. LPDDR4 DDR4  For more details, refer to the main mScale DDR tools page: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467 Please note that this page is only intended to store the RPA spreadsheets. For questions, please create a new community thread.  
View full article
From Android 12, NXP use GKI(Generl kernel image) instead of NXP's kernel code.  This follow up Android ASOP standard. This article described that when customer use Android 12 and later version, they need to pay attention on GKI development, which is different with previous version.
View full article
This is a summary for the software lockup issue found in the following platform: −i.MX8/8X −Linux 4.14.98_2.3.3   Issue description: •Issue happens during the boot procedure, at the systemd stage. •The symptom of the issue: −From user perspective, the symptom varies, but mainly fall into several types: §At the console, there may be login prompt, but no response (only echo) when input user/password. Unable to login. §Some user service in systemd failed to start. E.g. weston. −When checking the task status using sysrq (w/t), many tasks, including some kernel core tasks stays in “D” (uninterruptable sleep) state. E.g. agetty, login, chvt, etc. •Kernel itself is still alive. This can be verified by triggering some drivers, such as plugin a USB device. Issue can be reproduced on MEK through long time stress.   Please refer to the doc/patch attached for details.
View full article
PCIE IP on i.MX8MM and i.MX8MP is same, customer can follow PCIE test Application note to do compliance test, if eye diagram failed, they can fine turn corresponding regs below: iMX8MMRM.pdf IMX8MPRM.pdf GEN1:             GEN2:                 Related code in kernel Phy-fsl-imx8-pcie.c (kernel-source\drivers\phy\freescale)    3794      2020/11/4 static int imx8_pcie_phy_init(struct phy *phy) { ……          /* Configure TX drive level  */        writel(0x2d, imx8_phy->base + 0x404);          return 0; }   Thanks Lambert
View full article
BSP: L5.15.5_1.0.0   Platform: i.MX8MPlus EVK   1. Parameter preparation For more parameter calculation, please refer to: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX-8M- Mini-Register-Programming-Aid-DRAM-PLL-setting/ta-p/111209  For 1866MHz LPDDR4, we need a DRAM PLL size of 933MHz. The PLL dividing parameters are: m=622,p=16,s=0, k=0.   2. Calibration and stress test with DDR Tool 2.1 Creating a test script for 1866MHz Here we copy the script from another file (e.g. 2000MHz) and modify the contents of the script.   2.2 Modify the script to adapt to 1866MHz 2.3 Download the test script After selecting the ddr script we created, click on the download button   2.4 Calibrating the stress test Set the core clock of the chip's cpu to 1.2GHz, then click the Calibration button to calibrate, then click Gen Code to generate the lpddr4_timing.c file. Set the start frequency to 1866MHz for the stress test.   2.5 Modify lpddr4_timing.c We need to modify the generated lpddr4_timing.c file to change the maximum speed to 3732MTS.   3. SPL patch After getting the correct lpddr4_timing.c file, the SPL code also needs to be modified to add support for the 933MHz DRAM PLL. diff --git a/arch/arm/mach-imx/imx8m/clock_imx8mm.c b/arch/arm/mach-imx/imx8m/clock_imx8mm.c index e39f238fdf...5622a6334e 100644 --- a/arch/arm/mach-imx/imx8m/clock_imx8mm.c +++ b/arch/arm/mach-imx/imx8m/clock_imx8mm.c @@ -55,6 +55,7 @@ static struct imx_int_pll_rate_table imx8mm_fracpll_tbl[] = { PLL_1443X_RATE(650000000U, 325, 3, 2, 0), PLL_1443X_RATE(600000000U, 300, 3, 2, 0), PLL_1443X_RATE(594000000U, 99, 1, 2, 0), + PLL_1443X_RATE(933000000U, 622, 16, 0, 0), PLL_1443X_RATE(400000000U, 400, 3, 3, 0), PLL_1443X_RATE(2660000U, 266, 3, 3, 0), PLL_1443X_RATE(167000000U, 334, 3, 4, 0), diff --git a/drivers/ddr/imx/imx8m/ddrphy_utils.c b/drivers/ddr/imx/imx8m/ddrphy_utils.c index 326b92d784..ebd005bc2b 100644 --- a/drivers/ddr/imx/imx8m/ddrphy_utils.c +++ b/drivers/ddr/imx/imx8m/ddrphy_utils.c @@ -117,6 +117,10 @@ void ddrphy_init_set_dfi_clk(unsigned int drate) dram_pll_init(MHZ(1000)); dram_disable_bypass(); break; + case 3732: + dram_pll_init(MHZ(933)); + dram_disable_bypass(); + break; case 3200: dram_pll_init(MHZ(800)); dram_disable_bypass();   4. Test results   Reference blog. DDR Tool: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467  RPA: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8MPlus-m865S-DDR-Register-Programming-Aids-RPA/ta-p/1235352 
View full article
Hello, here Jorge. On this post I will explain how to configure, record and play audio using an i.MX 8MIC-RPI-MX8 Board. Requirements: I.MX 8M Mini EVK Linux Binary Demo Files - i.MX 8MMini EVK (L5.15.52_2.1.0) i.MX 8MIC-RPI-MX8 Board Serial console emulator (Tera Term, Putty, etc.) Headphones/speakers The 8MIC-RPI-MX8 accessory board is designed for voice enabled application prototyping and development on the i.MX 8M family. The board plugs directly into the 40-pin expansion connector on the i.MX 8M Mini and Nano EVK’s. Some features about this board are: 8 PDM Microphones 8 monochrome LEDs 4 multi-color LEDs 2 status LEDs 4 pushbuttons Microphone Mute Switch Microphone geometry switch Connecting the i.MX 8MIC-RPI-MX8 Board. The i.MX 8MIC-RPI-MX8 Board has a 40-pin expansion connector that you can plug it directly to the EVK board. Ensure that pin 1 of the 8MIC-RPI-MX8 is aligned with pin 1 on the EVK J1001 as is showed on the next figure:  Selecting the device tree on the board. Once the pre-compiled image is flashed on the board (Flashing Linux BSP using UUU) and you connected the 8MIC-RPI-MX8 it is necessary to select the correct device tree to handle 8MIC board. On U-boot check the available .dtb files on the BSP using the next command: u-boot=> fatls mmc 2:1 And you will get the corresponding list of .dbt files:  On this case we are working with an I.MX 8M Mini EVK and the corresponding .dtb file is: imx8mm-evk-8mic-revE.dtb To select it you need to set the environment variable and save it with: u-boot=> setenv fdtfile imx8mm-evk-8mic-revE.dtb u-boot=> saveenv Doble check it using: u-boot=> printenv fdtfile   Now it is time to boot Linux using the next command: u-boot=> boot Recording audio with the i.MX 8MIC-RPI-MX8 Board. The Advanced Linux Sound Architecture (ALSA) provides audio and MIDI functionality to the Linux operating system. ALSA has the following significant features: Efficient support for all types of audio interfaces, from consumer sound cards to professional multichannel audio interfaces. Fully modularized sound drivers. SMP and thread-safe design. User space library (alsa-lib) to simplify application programming and provide higher level functionality. Support for the older Open Sound System (OSS) API, providing binary compatibility for most OSS programs. Once we are on Linux, we can check our audio codecs detected on the board using: arecord -l   Now, to record audio we need to use the ALSA arecord command to start recording with IMX8 boards, there are different options that you can check on the next link. On this case we are going to use the next: arecord -D hw:imxaudiomicfil -c8 -f s16_le -r48000 -d10 sample.wav -D: selects the device. -c: selects the number of channels on the recording. -f: selects the format. -r: selects the sample rate. -d: determinate the duration recording time in seconds. sample.wav: Is the name of the resulting audio file. Running the last command, we started to record audio. It is time to make some noise and record it!   Playing audio from IMX8 boards. Now it is time to connect our headphones or speakers to the jack.   Also, as on arecord command you can check the devices where you can play audio from the board using the next command: aplay -l And you will get all the codecs to play audio:   To play our recordings we need to use the ALSA aplay command, it is important to select the correct audio codec to hear the audio from the jack on the board: aplay -Dplughw:3,0 sample.wav -D: selects the device. sample.wav: Is the name of audio file to play   Hope this will helpful for people who wants to record audio using PDM microphones and playing audio from IMX8 boards. Best regards.
View full article