Wireless Connectivity Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wireless Connectivity Knowledge Base

Discussions

Sort by:
This post explains the implementation to operate the KW36 MCU on VLPR when the clocking mode is BLPE or BLPI. It's also included the explanation on how to configure clocks for BLPE and BLPI modes. For this example, the beacon demo from the wireless examples of the FRDM-KW36 is used. FRDM-KW36 SDK can be downloaded from MCUXpresso webpage. A recommended option to configure clock modes is "Config Tools" from MCUXpresso. Config Tools is embedded to MCUXpresso IDE, or you can download Config Tools from this LINK if you are using other supported IDE for this tool. MCUXpresso IDE is used in this example. Configure BLPE or BLPI clocking modes Select your proyect on MCUXpresso IDE, then open the clocks configuration window from Config Tools by clicking the arrow next to Config Tools icon from your MCUXpresso IDE, and then select "Open Clocks" as shown in Figure 1. Figure 1. Open Clocks from Config Tools using MCUXpresso IDE. A clocks diagram window will be opened. To configure the clock modes just select your option "BLPI" or "BLPE" on MCG Mode as shown in Figure 2. Clock will be automatically configured. Figure 2. MCG Mode selection. Now let's configure the appropiate clocks for Core clock and Bus clock to run in VLPR. Figure 3 taken from KW36 Reference Manual shows achievables frequencies when MCU is on VLPR.  Figure 3. VLPR clocks. Core clock should be 4MHz for BLPE and BLPI clocking modes, and Bus clock should be 1MHz for BLPE and 800kHz for BLPI.  Figure 4 shows clocks distribution for BLPE and Figure 5 for BLPI to operate with discussed frequencies. Figure 4. Clock distribution - VLPR and BLPE. Figure 5. Clock distribution - VLPR and BLPI. Press "Update Project" (Figure 6) to apply your new clock configuration to your firmware, then change perspective to "Develop" icon on right corner up to go to your project (See Figure 7). Compile your project to apply the changes. Figure 6. Update Project button. Figure 7. Develop button. At this point your project is ready to work with BLPE or BLPI clocks modes. Now, let's configure MCU to go to VLPR power mode. Configure VLPR mode VLPR mode can be configured using Config Tools too, but you may have an error trying to configure it when BLPE mode, this is because CLKDIV1 register cannot be written when the device is on VLPR mode. For this example, let's configure MCU into VLPR mode by firmware. Follow next steps to configure KW36 into VLPR power mode: 1. Configure RF Ref Oscillator to operate in VLPR mode. By default, the RF Ref Osc it's configured to operate into RUN mode. To change it to operate on VLPR mode just change the bits RF_OSC_EN from Radio System Control from 1 (RUN) to 7 (VLPR). Figure 8 taken from KW36 Reference Manual shows RF_OSC_EN value options from Radio System Control.    Figure 8. RF_OSC_EN bits from Radio System Control register. Go to clock_config.c file in your MCUXpresso project and search for "BOARD_RfOscInit" function. Change the code line as shown in Figure 9 to configure RF Ref Osc to work into VLPR mode. You may see a window asking if you want to make writable the read-only file, click Yes. Figure 9. Code line to configure RF Ref Osc to work into VLPR mode Be aware that code line shown in Figure 9 may change with updates done in clocks using Config Tools. Note 2. Configure DCDC in continuous mode. According to KW36 Reference Manual, the use of BLPE in VLPR mode is only feasible when the DCDC is configured for continuous mode. First, let's define gDCDC_Enabled_d flag to 1 on preprocesor. With this implementation, the use of DCDC_Init function will be enabled, and it's where we going to add the code line to enable continuous mode. Right click on your project, select Properties, go to Settings under C/C++ Build, then Preprocessor under MCU C Compiler (Figure 10).   Figure 10. MCUXpresso Preprocessor   Click on add button from Defined symbols, write gDCDC_Enabled_d=1 and click OK to finish (Figure 11).  Re-compile your project. Figure 11. MCUXpresso Defined symbols   Now let's set VLPR_VLPW_CONFIG_DCDC_HP bits to 1 from DCDC_REG0 register. Figure 12 was taken from KW36 Reference Manual. Figure 12. VLPR_VLPW_CONFIG_DCDC_HP values. Go to DCDC_Init  function and add the next code line to enable continuous mode on DCDC: DCDC->REG0 |= DCDC_REG0_VLPR_VLPW_CONFIG_DCDC_HP_MASK; Figure 13 shows the previous code line implemented in firmware project inside of DCDC_Init function. Figure 13. Continuous mode for DCDC enabled. 3. Configure MCU into VLPR mode To finish, let's write the code to configure MCU into VLPR power mode. Copy and paste next code just after doing implementation described on step 1 and 2: #if (defined(FSL_FEATURE_SMC_HAS_LPWUI) && FSL_FEATURE_SMC_HAS_LPWUI) SMC_SetPowerModeVlpr(SMC, false); #else SMC_SetPowerModeVlpr(SMC); #endif while (kSMC_PowerStateVlpr != SMC_GetPowerModeState(SMC)) { } It may be needed to add the SMC library: #include "fsl_smc.h" The code is configuring MCU into VLPR mode with bits RUNM from SMC_PMCTRL register (Figure 14) and then check if it was correctly configured by reading status bits PMSTAT from SMC_PMSTAT register (Figure 15) Figure 14. RUNM bits from SMC_PMCTRL register. Figure 15. PMSTAT bits from  SMC_PMSTAT register. KW36 is ready to operate and BLPE or BLPI clocking modes with VLPR power mode.
View full article
With the release of the Bluetooth LE core erratum 10734, two new Host test cases (SM/SLA/KDU/BI-01-C and SM/MAS/KDU/BI-01-C) were added to the Test Case Reference List (TCRL) and are active since 24-Jan-19. This has an impact on new product qualifications based on Component (Tested) QDIDs that used an older TCRL when the test cases for this erratum were not required. Products that rely on NXP HOST QDIDs have 2 options for covering the erratum 10734 in order to complete the qualification: NXP provides a new qualification/QDID that includes these 2 tests. This is scheduled for later this year for QN908x, KW35/36 and KW41/31 products. NXP provides the test evidence/logs for these 2 tests and the test house reviews them before completing the product qualification. Right now, option 2 can be followed using the test evidence/logs provided by NXP. Later in the year, option 1 can be followed with an updated QDID. To obtain the test evidence/logs, please submit a support request.
View full article
Wireless Equipment: Ellisys:  Ellisys is a leading worldwide supplier of advanced protocol test solutions for Bluetooth®, Wi-Fi, WPAN, USB 2.0, SuperSpeed USB 3.1, USB Power Delivery, USB Type-C, DisplayPort and Thunderbolt technologies.  USB, Bluetooth and WiFi Protocol Test Solutions  Bluetooth Vanguard - Advanced Bluetooth Analysis System Bluetooth Qualifier - Bluetooth Qualification System   RFcreations:     RFcreations is a core team of highly skilled and knowledgeable, professional engineers with decades of experience across the design and development of both RF and digital hardware, embedded, protocol stacks and UI software mini-moreph morephCS   Teledyne Lecroy:    offers an extensive range of test solutions to help with design, development, and deployment of devices and systems frontline-x240 Wireless Protocol Analyzer  frontline-x500e Wireless Protocol Analyzer  Rohde&Schwarz:        is a global technology group striving for a safer and connected world. Offers Test & Measurement, Technology Systems and Networks & Cybersecurity Divisions R&S CMW270 wireless connectivity tester Useful links:  Top Online Bluetooth LE learning Resource Ellisys Bluetooth Video Series RFcreations Bluetooth Sniffers and Test Tools Learn Bluetooth Low Energy in a single weekend
View full article
The KW43 product family is a low-power, secure, single-chip wireless MCU that integrates a high performance, Bluetooth Low Energy, Bluetooth Channel Sounding, EdgeLock Secure Accelerators, and various MCU peripherals targeted for Automotive applications. The KW43 family utilizes an Arm® Cortex®-M33 core (Armv8-M architecture) running up to 96 MHz for customer applications. The family includes memory configurations of up to 1.5MB flash and 256 KB SRAM across all listed part numbers. All devices in the family integrate a state-of-the-art, scalable security architecture including Arm’s TrustZone®-M, a resource domain controller and an isolated EdgeLock Secure Accelerators supporting hardware cryptographic accelerators, random number generators and key generation, storage, and management along with secure debug. All members of the KW43 family are designed to be compliant to a SESIP Level 3 certification following the Arm PSA Level 3 profile. KW43 uses dual Arm Core Cortex-M33 (‘CM33’) and supports multiple interfaces and security features. One is for application and system use and other is for radio link layer and both cores share a common flash of 1.5 MB. The devices include a full certified Bluetooth LE 6.x controller stack with support for up to 10 simultaneous connections in any controller/peripheral combination. The multiprotocol radio subsystem integrated in the KW43 Family is energy efficient and is designed for Wi-Fi coexistence. The radio is supported with tested software stacks for Bluetooth Low Energy for standalone and hosted applications to enable a range of Automotive, IoT and industrial applications. There is also software and hardware support for 2.4 GHz proprietary protocols. To address ranging requirements, the Localization Engine (LCE) is integrated into the system for enhanced localization performance. The KW43 series is supported by the MCUXpresso Developer Experience to optimize, ease and help accelerate embedded system development. Early access program The KW43 is in pre-production, developers can get started today with the KW45/KW47, which is pin and software compatible.   you can request access contacting NXP sales team - Pascal Bernard ([email protected]) Join KW47 early access program here: KW43 Early Access Training Bluetooth Low energy 6.0 NXP Introduction Interested in Bluetooth technology? Bluetooth® Low Energy Primer – Essential reading for understanding BLE fundamentals. Bluetooth® Specifications – Full list of standards, protocols, and technical documents. Awards and Recognition - Every year, the Bluetooth Special Interest Group (SIG) celebrates the hard work and commitment of working groups, committee members, and contributors who have been recognized by their peers as making a difference in advancing Bluetooth technology.  2024: Channel Sounding 2025: Channel sounding amplitude-based attack resilience, LE test mode enhancements and Ranging profile and service.  Bluetooth Feature Overview Bluetooth_5.0_Feature_Overview  Bluetooth_5.1_Feature_Overview  Bluetooth_5.2_Feature_Overview Bluetooth_5.3_Feature_Overview Bluetooth_5.4_Feature_Overview Bluetooth_6_Feature_Overview Bluetooth_6.1_Feature_Overview Bluetooth_6.2_Feature_Overview Bluetooth_6.3_Feature_Overview RF Switch Comparison Absorptive/Reflective Standards Comparison ETSI / FCC / ARIB requirements BLE Channel Sounding  - Overview BLE Channel Sounding - RF Hardware BLE Channel Sounding - ANSYS Modeling Tools  BLE Channel Sounding - Antenna Prototypes Validation Measurements Equipment Wireless Equipment: This article provides the links to the Equipment that helps to the project development  Useful Links How to import and run demo examples with MCUXpresso for Visual Studio Code: This article gives information on how to import and run demo examples from the new SDK with ARM GCC toolchain, in MCUXpresso for Visual Studio Code. [MCUXSDK] How to use GitHub SDK for KW4x, MCXW7x, MCXW2x - NXP Community this community post provides step by step how to use GitHub SDK [MCUXSDK] GitHub SDK - Documentation for Bluetooth LE platforms - NXP Community this community post provides the documentation for BLE platforms.  How to use the HCI_bb on Kinetis family products and get access to the DTM mode:  This article is presenting two parts: How to flash the HCI_bb binary into the Kinetis product. Perform RF measurement using the R&S CMW270 BLE HCI Application to set transmitter/receiver test commands: This article provides the steps to show how user could send serial commands to the device. Bluetooth LE HCI Black Box Quick Start Guide: This article describes a simple process for enabling the user controls the radio through serial commands.
View full article
Board pictures (KW47-M2) neidys_vargas_0-1753807293929.png Connectors (KW47-M2) Part Identifier Connector Type Description J3 2x5 pin header SWD DNP J8 1x6 pin header UART1 – FTDI DNP J9 1x6 pin header Power connector DNP Jumpers (KW47-M2) Part Identifier Connector Type Description JP5 2x3 pin header supply power source selection jumper: 1-2 shorted (default configuration): Use this configuration to set target MCU in DCDC mode.  3-4 shorted: Use this configuration to set target MCU in LDO/Bypass mode. All MCU power domains are supplied by P3V3_DUT.  JP4 1x2 pin header Target MCU boot configuration enable jumper: • Open (default setting): ISP mode is disabled • Shorted: ISP mode is enabled Push Buttons (KW47-M2) Part Identifier Switch name Description SW1 Reset button Resets the target MCU. This causes peripherals to reset to their default state. After this, MCU ROM bootloader will be executed. LED D1 turns on at SW1 press. SW2 User PB General purpose input. This pin supports low-power wakeup capabilities through Wake-Up Unit (WUU). LEDs (KW47-M2) Part Identifier Switch name Description D1 Reset LED Indicates a system reset event. When reset is triggered—such as by pressing the SW1 reset button—the D1 LED turns ON. D2 Led Green User indicator, indicates system activity   Power Configurations (KW47-M2) Populate J9 PWR connector. To run KW47 M2 as standalone, supply 3.3V to P3V3_DUT power rail neidys_vargas_1-1753714061544.png Figure 1 J9 M10 Configuration (KW47-M2)   To get the KW47 M2 up and running, you need to select a power configuration through JP5 jumper. For more information on KW47 power configurations, refer to RM: Part Identifier pin Description JP5 1-2 1-2 shorted (default setting): Sets target MCU to DCDC mode. This mode is the recommended configuration. JP5 3-4 3-4 shorted: Sets target MCU to LDO mode.     External power configuration (KW47-M2) Enable KW47-M2 by supplying power through J9 connector: Note: When using DCDC or LDO mode, it is recommended to supply P3V3_DUT power rail only. Part Identifier pin Description J9 5 Use this pin to supply P3V3_DUT power rail with 3.3V. To get KW47-M2 up and running, it is recommended to set KW47 to DCDC mode and supply P3V3_DUT only. J9 3 Use this pin to supply P1V8_LDO power rail with 1.8V. This power rail is intended for an accurate control of VDD_RF power domain, but it is not necessary. J9 1 Use this pin to supply P1V1_EXT power rail with 1.1V. This power rail is intended for an accurate control of VDD_CORE power domain, but it is not necessary.   neidys_vargas_2-1753714061554.png   Programming the NBU in the KW47-M2 board The following steps guide you to program the NBU software for the KW47-M2 Place a jumper on the JP4 header while holding down the reset button (SW) on the module board. Then, connect the USB cable to the J8 connector (USB-to-serial bridge) and plug it into your computer. After the USB cable is connected, release the reset button. neidys_vargas_6-1753714061702.png   Verify what COM Port was assigned to your KW47-M2 board. You can check the COM Port assigned in the Windows “Device Manager” program. Search for “Ports (COM & LPT)” and save the COM Port number. In this example the COM Port assigned was “COM19” neidys_vargas_7-1753714061704.png   Navigate to your computer to the MCU-Link installation folder. The default installation path is located at “C:\nxp\LinkServer_25.3.31\MCU-LINK_installer Locate the “bin” folder and open it. Run the script “blhost” within a windows command prompt. neidys_vargas_8-1753714061713.png   Type “blhost.exe -p COMX write-memory 0x48800000”, drag and drop the NBU binary file. When the process is ready you will see the response status "success" neidys_vargas_9-1753714061729.png  
View full article
The connectivity software is an add-on of the Kinetis SDK, therefore the demos are referenced to a KSDK path variable named "KSDK_PATH" in IAR. The KSDK_PATH variable contains the path of the installation folder for the KSDK version in your PC. Taking as an example the MRB-KW01 SMAC Connectivity Software, we can realize that this variable is used to reference for libraries. In particular, this SMAC software for the MRB-KW01 works with KSDK 1.2, that is why you could have troubles if the variable is referenced to another KSDK version (for example KSDK 1.1). Follow the next steps to modify the KSDK_PATH variable in your computer: 1. Right click on "computer", then click "properties" 2. A Control Panel window will be opened. Click on "Advanced system settings" 3. A system Properties windows will be opened. Select the "Advanced" tab, then click "Environment Variables". 4. Select the KSDK_PATH variable and assure that it stores the correct path needed for your project. In case that you need to modify the variable, then click "Edit" 5. Finally click "Ok" to close all tabs and you will be able to run your connectivity software without problems. Best regards, Luis Burgos.
View full article
Introduction In some applications, is it necessary to keep updated the software running in many MCU's that take part in the system, fortunately, Over The Air Programming, it's a custom Bluetooth LE service developed to send "over the air" software updates for the KW MCU series. FRDM-KW36 SDK already provides the "otap_client" software, that can be used together with the "otap_bootloader" such as it is described in the following community post: Reprogramming a KW36 device using the OTAP Client Software to reprogram the KW36. This example can be modified to store code for another MCU and later send the software update to this device as depicted in the figure below. This post guides you on modifying the OTAP client software to support software updates for other MCU's. Preparing the OTAP client software The starting point of the following modifications is supposing that there is no need to perform over the air updates for the KW36 MCU, so the use of the "otap_bootloader" is obsolete and will be removed in this example. In other words, KW36 will be programmed only with the "otap_client" code. Open the MCUXpresso settings window (Project->Properties->"C/C++ Build->MCU settings") and configure the following fields. Save the changes. For external storage: For internal storage: Locate the "app_preinclude.h" file, and set the storage method, as follows: For external storage: #define gEepromType_d       gEepromDevice_AT45DB041E_c For internal storage: #define gEepromType_d        gEepromDevice_InternalFlash_c Locate the "main_text_section.ldt" linker script into the "linkscripts" folder, and delete it from the project.  Search in the project for "OTA_SetNewImageFlag();" and "ResetMCU();" functions in the "otap_client.c" file (source->common->otap_client->otap_client.c) and delete or comment. (For reference, there are 4 in total). Locate the following code in "OtaSupport.h" (framework->OtaSupport->Interface) and delete or comment. extern uint16_t gBootFlagsSectorBitNo;‍‍‍‍‍‍ void OTA_SetNewImageFlag(void);‍‍‍‍‍‍‍ Locate the following code in "OtaSupport.c" (framework->OtaSupport->Source) and delete or comment. extern uint32_t __BootFlags_Start__[]; #define gBootImageFlagsAddress_c ((uint32_t)__BootFlags_Start__)‍‍‍‍‍‍‍‍‍‍‍‍ #if !gEnableOTAServer_d || (gEnableOTAServer_d && gUpgradeImageOnCurrentDevice_d) /*! Variables used by the Bootloader */ #if defined(__IAR_SYSTEMS_ICC__) #pragma location = "BootloaderFlags" const bootInfo_t gBootFlags = #elif defined(__GNUC__) const bootInfo_t gBootFlags __attribute__ ((section(".BootloaderFlags"))) = #elif defined(__CC_ARM) volatile const bootInfo_t gBootFlags __attribute__ ((section(".BootloaderFlags"))) = #else #error "Compiler unknown!" #endif { {gBootFlagUnprogrammed_c}, {gBootValueForTRUE_c}, {0x00, 0x02}, {gBootFlagUnprogrammed_c}, #if defined(CPU_K32W032S1M2VPJ_cm4) && (CPU_K32W032S1M2VPJ_cm4 == 1) {PLACEHOLDER_SBKEK}, {BOOT_MAGIC_WORD} #endif }; #endif /* !gEnableOTAServer_d || (gEnableOTAServer_d && gUpgradeImageOnCurrentDevice_d) */‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ uint16_t gBootFlagsSectorBitNo; gBootFlagsSectorBitNo = gBootImageFlagsAddress_c/(uint32_t)((uint8_t*)FSL_FEATURE_FLASH_PFLASH_BLOCK_SECTOR_SIZE);‍‍‍‍ gBootFlagsSectorBitNo = gBootImageFlagsAddress_c/(uint32_t)((uint8_t*)FSL_FEATURE_FLASH_PAGE_SIZE_BYTES);‍‍‍‍ void OTA_SetNewImageFlag(void) { #if (gEepromType_d != gEepromDevice_None_c) && (!gEnableOTAServer_d || (gEnableOTAServer_d && gUpgradeImageOnCurrentDevice_d)) /* OTA image successfully written into the non-volatile storage. Set the boot flag to trigger the Bootloader at the next CPU Reset. */ union{ uint32_t value; uint8_t aValue[FSL_FEATURE_FLASH_PFLASH_BLOCK_WRITE_UNIT_SIZE]; }bootFlag; #if defined(CPU_K32W032S1M2VPJ_cm4) && (CPU_K32W032S1M2VPJ_cm4 == 1) uint8_t defaultSBKEK[SBKEK_SIZE] = {DEFAULT_DEMO_SBKEK}; #endif uint32_t status; if( mNewImageReady ) { NV_Init(); bootFlag.value = gBootValueForTRUE_c; status = NV_FlashProgramUnaligned((uint32_t)&gBootFlags.newBootImageAvailable, sizeof(bootFlag), bootFlag.aValue); if( (status == kStatus_FLASH_Success) && FLib_MemCmpToVal(gBootFlags.internalStorageAddr, 0xFF, sizeof(gBootFlags.internalStorageAddr)) ) { bootFlag.value = gEepromParams_StartOffset_c + gBootData_ImageLength_Offset_c; status = NV_FlashProgramUnaligned((uint32_t)&gBootFlags.internalStorageAddr, sizeof(bootFlag), bootFlag.aValue); } #if defined(CPU_K32W032S1M2VPJ_cm4) && (CPU_K32W032S1M2VPJ_cm4 == 1) if( status == kStatus_FLASH_Success ) { /* Write the default SBKEK for secured OTA */ status = NV_FlashProgramUnaligned((uint32_t)&gBootFlags.sbkek, SBKEK_SIZE, defaultSBKEK); } #endif if( status == kStatus_FLASH_Success ) { mNewImageReady = FALSE; } } #endif }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   At this point, the FRDM-KW36 can receive and store any image for any MCU and can request a further software update from the OTAP server device.    Adding API's to reprogram the "MCU X" on OTAP client software Once the software update has been downloaded from the OTAP Server into the OTAP Client, the developer should request the software update from the OTAP Client to the "MCU X" through a serial protocol such as UART, SPI, CAN, etc. You should develop the API's and the protocol according to the requirements for your system to send the software update to the "MCU X" (as well as the bootloader for the MCU X). The handling your protocol can be integrated into the OTAP client code replacing "ResetMCU()" (The same code removed in step 4) in the code by "APISendSoftwareUpdateToMCUX()" for instance, since at this point the image was successfully sent over the air and stored in the memory of the KW36. 
View full article
Matter is the industry-unifying standard from the Connectivity Standards Alliance that is delivering reliable, secure and interoperable connectivity for smart home devices, ensuring that they will work seamlessly together, today and tomorrow. From connectivity to security, processing and software, NXP offers complete end-to-end solutions for accelerating the development of Matter-enabled devices and is focused on helping our customers overcome the complexity and challenges that come with developing around this game-changing technology.   Getting Started Our investment in Matter starts with easing the development experience for adopting Matter in existing or new designs. With the breadth and scale of our portfolios, we scale to the system level to enable the autonomous edge - bringing intelligence to the edge. This approach provides developers with integrated platforms for the processing, connectivity and security requirements to go from prototype to production faster.   Matter Open-Source Protocol Compatible Products    Matter (previously known as Project CHIP) is a single, unified, application-layer connectivity standard designed to enable developers to connect and build reliable, secure IoT ecosystems and increase compatibility among Smart Home and Building devices. Backed by major brands and developed through collaboration within the Connectivity Standards Alliance (previously known as the Zigbee Alliance), Matter is an open-source royalty-free connectivity standard built with market-proven technologies using Internet Protocol (IP) and compatible with Thread and Wi-Fi network transports.   Useful Links   Getting Started with MCUXpresso for VS Code: Matter on Windows (24.12.71) MCUXpresso extension for VS Code v24.12.71 integrates the Matter toolchain for development on Windows, macOS and Linux.    Understanding Matter Terminology   Matter Is What's Cooking and NXP Has All the Right Ingredients     Matter GitHub Links    Releases Matter 
View full article
KW01 demo code for 315/434MHz application is ready. The demo code located in the "software Development Tools" FXTH87|Tire Pressure Monitor Sensor|Freescale
View full article
Regarding to the "Reprogramming a KW36 device using the OTAP Client Software" and "Reprogramming a KW35 device using the OTAP Client Software" documents, there are some additional steps to debug the OTAP client software in the specific case when you use MCUXpresso together with a P&E micro debug probe. Just before to program the OTAP client project (the second software), the user must do the following: Open the "Debug Configurations" view clicking on the green bug as depicted below. Go to the "Debugger" perspective and search the "Advanced Options" button. Enable the "Preserve this range (Memory Range 0)" checkbox, and edit the textbox "From: 0" To: 1fff" for the KW36 device or "From: 0 To: 3fff" for the KW35 device. After to flash the device, disconnect and connect again. If everything it's OK, the RGB LED must blink (If you are using an FRDM board). Then, test the demo as described in the document.
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-340993
View full article
View the Webinar Recording
View full article
The customer wanted to update the FW of the PN7462 to an NFC cockpit. In general, we recommend that customers use MASS STORAGE MODE to update two files (including Flash and EEPROM) into memory. But there will always be customers who don’t know or how to successfully access MASS STORAGE MODE. They cannot succeed in doing so. Therefore, it is recommended to use the GUI FLASH tool to upgrade the FW to the NFC cabin. In order to clearly indicate the user how to use the GUI FLASH tool, this document describes this step by step.
View full article
See the necessary steps to enable additional SDK components for a project when using GitHub SDK and Kconfig/CMake.
View full article
    As the support for MCUXpresso IDE as GUI and toolchain will be stopped and will be replaced by MCUXpresso for Visual Studio Code, I am sharing here some essential steps to start development on Visual Studio Code and MCUXpresso plugin. Preparation: - MCUXpresso for VS Code is installed as an extension inside Microsoft VS Code - see https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-for-visual-studio-code:MCUXPRESSO-VSC - The rest of the toolchain including ARMGCC, west and other tools which work with MCUX for VS Code installation is available via MCUXpresso SDK option of the MCUXpresso Installer: https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-installer:MCUXPRESSO-INSTALLER - See also generic Getting Started Guide for MCUX SDK with MCUX for VS Code at: https://mcuxpresso.nxp.com/mcuxsdk/latest/html/gsd/run_a_demo_using_mcuxvsc.html   Here I will provide the procedure to import the loc_reader example from the repository.   Import the repository: The recommended approach is to import REMOTE ARCHIVE which has a similar environment as the legacy MCUXpresso IDE. Here I will provide the procedure to import the loc_reader example from the repository From the MCUXpresso plugin, select "Import Repository", then in the "REMOTE ARCHIVE" tab, select the board, the SDK version and the location: import.png Wait for the repository to be imported, this procedure can take several minutes. Once the import is succeed, it will appear here: imported.png Import demo projects and run: Once the repository is successfully imported, you can then import demo examples from the repo by selecting "Import Example from Repository": project import.pngthen select the demo example from "Template". "AppType" should be "Freestanding application" if you want a standalone project. "Location" is where the project will be located.  "Toolchain" should be the Arm GNU one that you installed in preparation steps Build and run the imported project: build and run.png  
View full article
By default, FRDM-KW36 board includes a 32MHz XTAL (YI) as shown in Figure 1 but there are cases where a 26MHz XTAL is needed instead of 32MHz XTAL for FRDM-KW36 or a custom KW36 board.   Figure 1. 32MHz XTAL from FRDM-KW36 schematics Wireless connectivity demos from FRDM-KW36 Sofware Development Kit are configured to run with a 32MHz XTAL by default, but it's very easy to modify the software to operate with a 26MHz XTAL. Follow next steps to configure a FRDM-KW36 wireless connectivity demo to operate with a 26MHz XTAL: 1. In clock_config.h file, change BOARD_XTAL0_CLK_HZ define from 32000000U to 26000000U as shown in Figure 2.   Figure 2. BOARD_XTAL0_CLK_HZ define in clock_config.h 2. Add RF_OSC_26MHZ=1 line in preprocessor: If using IAR IDE: Right click on your project, then click options (Figure 3). Figure 3. IAR project options Go to C/C++ Compiler tab, then Preprocessor, and add RF_OSC_26MHZ=1 line in defined symbols window (Figure 4). Figure 4. IAR Preprocessor If using MCUXpresso IDE: Right click on your project, select Properties, go to Settings under C/C++ Build, then Preprocessor under MCU C Compiler (Figure 5). Figure 5. MCUXpresso Preprocessor Click on add button from Defined symbols, write RF_OSC_26MHZ=1 and click OK to finish (Figure 6). Figure 6. MCUXpresso Defined symbols To finish, re-compile your project and it will be ready to operate with a 26MHz XTAL. FRDM-KW36 SDK can be downloaded from the MCUXpresso webpage.
View full article
This video shows how to load the Open SDA software from PE micro to the TWR-KW2x in order to debug applications using USB port and without needing external JTAG debuggers. Required downloads: TWR-KW2x Board Support Package:Kinetis KW2x Tower System Modules|Freescale PE Micro - Open SDA: P&E Microcomputer Systems
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-340508
View full article
In daily work, many customers are asking how to develop Mifare Desfire EV3. Yes, it is true that the Mifare Desfire EV3 is a highly secure product, and the related application documents are complicated and difficult for customers to use or take too much time to research, so I want to share them with you.
View full article