Wireless Connectivity Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wireless Connectivity Knowledge Base

Discussions

Sort by:
Most available example applications use UART as the serial interface for terminal communication. This approach is commonly chosen because a terminal provides a simple and efficient method for interacting with the application during development and debugging. The KW47-EVK supports two CAN/CAN-FD interface; as well as two UART interfaces accessible through the onboard USB-to-UART bridge.  The corresponding SoC peripheral instances are CAN0 and CAN1 for the CAN/CAN‑FD interfaces, and LPUART0 and LPUART1 for the UART interfaces. Since the LPUART1 serial interface and the CAN1 interface are routed to the same pins (PTC2 and PTC3) at the board level, and both functions can be enabled through header configuration, external isolation is required to ensure correct operation and prevent interference from other onboard components. If CAN1 must be enabled and your application also requires a serial terminal interface, then LPUART0 must be used as the serial interface.To enable both CAN1 and LPUART0 on the KW47‑EVK, follow the steps below: Changes required on hardware CAN Node A CAN Node B Pin name Board jumper Pin name Board jumper CANH J21 - 1 CANH J21 - 1 CANL J21 - 2 CANL J21 - 2 GND J21 - 4 GND J21 - 4 P12V J21 - 3 P12V J21 - 3  Note: Plug in the 12V power supply on J9 to supply the P5V_CAN. LPUART0 interface connection Functionality Board jumper Connection configuration LIN_RX JP11 2 - 3 LIN_TX JP12 2 - 3 UART_RX_USB selector JP16 2 - 3 UART_TX_USB selector JP17 2 - 3 CAN_RX_1 selector JP56 1 - 2 CAN_TX_1 selector JP57 1 - 2   Changes required on software Note: These steps assume you are using a FlexCAN SDK example application. If your application requires enabling CAN1 instead of the default CAN0, update the following configuration in your project’s source code: 1. In board.c, modify the LPUART instance, kCLOCK_Lpuart1 -> kCLOCK_Lpuart0: /* Initialize debug console. */ void BOARD_InitDebugConsole(void) { uint32_t uartClkSrcFreq = 0U; /* Set LPUART0 clock source */ CLOCK_SetIpSrc(kCLOCK_Lpuart0, kCLOCK_IpSrcFro192M); uartClkSrcFreq = CLOCK_GetIpFreq(kCLOCK_Lpuart0); DbgConsole_Init(BOARD_DEBUG_UART_INSTANCE, BOARD_DEBUG_UART_BAUDRATE, BOARD_DEBUG_UART_TYPE, uartClkSrcFreq); } 2. In board.h, modify the LPUART instance definitions: BOARD_DEBUG_UART_BASEADDR LPUART1 -> LPUART0 BOARD_DEBUG_UART_INSTANCE 1U -> 0U BOARD_DEBUG_UART_CLK_FREQ kCLOCK_Lpuart1 -> kCLOCK_Lpuart0 /* The UART to use for debug messages. */ #define BOARD_USE_LPUART #define BOARD_DEBUG_UART_TYPE kSerialPort_Uart #define BOARD_DEBUG_UART_BASEADDR (uint32_t) LPUART0 #define BOARD_DEBUG_UART_INSTANCE 0U #define BOARD_DEBUG_UART_CLK_FREQ (CLOCK_GetIpFreq(kCLOCK_Lpuart0)) 3. In hardware_init.c, modify the CAN instance to CAN1 at FlexCAN functional clock configuration: void BOARD_InitHardware(void) { BOARD_InitPins(); BOARD_BootClockRUN(); BOARD_InitDebugConsole(); /* FRO192M is configured as CAN1 functional clock in this example but other clock options may be available */ CLOCK_SetIpSrc(kCLOCK_Can1, kCLOCK_IpSrcFro192M); CLOCK_SetIpSrcDiv(kCLOCK_Can1, kSCG_SysClkDivBy1); } 4. In app.h, modify the EXAMPLE_CAN definition to CAN1: #define EXAMPLE_CAN CAN1 #define USE_CANFD (1) #define RX_MESSAGE_BUFFER_NUM (0) #define TX_MESSAGE_BUFFER_NUM (1) 5. In pin_mux.c, modify pin multiplexing configuration to enable CAN1 and LPUART0 pins respectively. You can copy and paste the below code to replace BOARD_InitPins function: void BOARD_InitPins(void) { /* Clock Config: Peripheral clocks are enabled; module does not stall low power mode entry */ CLOCK_EnableClock(kCLOCK_PortA); CLOCK_EnableClock(kCLOCK_PortC); const port_pin_config_t porta16_pin11_config = {/* Internal pull-up/down resistor is disabled */ (uint16_t)kPORT_PullDisable, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as LPUART0_RX */ (uint16_t)kPORT_MuxAlt6, /* Does not invert */ (uint16_t)kPORT_InputNormal, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTA16 (pin 11) is configured as LPUART0_RX */ PORT_SetPinConfig(PORTA, 16U, &porta16_pin11_config); const port_pin_config_t porta17_pin12_config = {/* Internal pull-up/down resistor is disabled */ (uint16_t)kPORT_PullDisable, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as LPUART0_TX */ (uint16_t)kPORT_MuxAlt6, /* Does not invert */ (uint16_t)kPORT_InputNormal, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTA17 (pin 12) is configured as LPUART0_TX */ PORT_SetPinConfig(PORTA, 17U, &porta17_pin12_config); const port_pin_config_t portc2_pin39_config = {/* Internal pull-up/down resistor is disabled */ (uint16_t)kPORT_PullDisable, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as CAN1_RX */ (uint16_t)kPORT_MuxAlt11, /* Does not invert */ (uint16_t)kPORT_InputNormal, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTC2 (pin 39) is configured as CAN1_RX */ PORT_SetPinConfig(PORTC, 2U, &portc2_pin39_config); const port_pin_config_t portc3_pin40_config = {/* Internal pull-up/down resistor is disabled */ (uint16_t)kPORT_PullDisable, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as CAN1_TX */ (uint16_t)kPORT_MuxAlt11, /* Does not invert */ (uint16_t)kPORT_InputNormal, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTC3 (pin 43) is configured as CAN1_TX */ PORT_SetPinConfig(PORTC, 3U, &portc3_pin40_config); } Run your demo application Connect a USB cable between the host PC and the KW47-EVK board J14. Open a serial terminal on PC for each board with the following settings: 115200 baud rate 8 data bits No parity One stop bit No flow control Download the program to the target board Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
View full article
The KW43 product family is a low-power, secure, single-chip wireless MCU that integrates a high performance, Bluetooth Low Energy, Bluetooth Channel Sounding, EdgeLock Secure Accelerators, and various MCU peripherals targeted for Automotive applications. The KW43 family utilizes an Arm® Cortex®-M33 core (Armv8-M architecture) running up to 96 MHz for customer applications. The family includes memory configurations of up to 1.5MB flash and 256 KB SRAM across all listed part numbers. All devices in the family integrate a state-of-the-art, scalable security architecture including Arm’s TrustZone®-M, a resource domain controller and an isolated EdgeLock Secure Accelerators supporting hardware cryptographic accelerators, random number generators and key generation, storage, and management along with secure debug. All members of the KW43 family are designed to be compliant to a SESIP Level 3 certification following the Arm PSA Level 3 profile. KW43 uses dual Arm Core Cortex-M33 (‘CM33’) and supports multiple interfaces and security features. One is for application and system use and other is for radio link layer and both cores share a common flash of 1.5 MB. The devices include a full certified Bluetooth LE 6.x controller stack with support for up to 10 simultaneous connections in any controller/peripheral combination. The multiprotocol radio subsystem integrated in the KW43 Family is energy efficient and is designed for Wi-Fi coexistence. The radio is supported with tested software stacks for Bluetooth Low Energy for standalone and hosted applications to enable a range of Automotive, IoT and industrial applications. There is also software and hardware support for 2.4 GHz proprietary protocols. To address ranging requirements, the Localization Engine (LCE) is integrated into the system for enhanced localization performance. The KW43 series is supported by the MCUXpresso Developer Experience to optimize, ease and help accelerate embedded system development. Early access program The KW43 is in pre-production, developers can get started today with the KW45/KW47, which is pin and software compatible.   you can request access contacting NXP sales team - Pascal Bernard ([email protected]) Join KW47 early access program here: KW43 Early Access Training Bluetooth Low energy 6.0 NXP Introduction Interested in Bluetooth technology? Bluetooth® Low Energy Primer – Essential reading for understanding BLE fundamentals. Bluetooth® Specifications – Full list of standards, protocols, and technical documents. Awards and Recognition - Every year, the Bluetooth Special Interest Group (SIG) celebrates the hard work and commitment of working groups, committee members, and contributors who have been recognized by their peers as making a difference in advancing Bluetooth technology.                2024: Channel Sounding              2025: Channel sounding amplitude-based attack resilience, LE test mode enhancements and Ranging profile and service.  Bluetooth AI Assistant - Amber Bluetooth Feature Overview Bluetooth_5.0_Feature_Overview  Bluetooth_5.1_Feature_Overview  Bluetooth_5.2_Feature_Overview Bluetooth_5.3_Feature_Overview Bluetooth_5.4_Feature_Overview Bluetooth_6_Feature_Overview Bluetooth_6.1_Feature_Overview Bluetooth_6.2_Feature_Overview Bluetooth_6.3_Feature_Overview Bluetooth Core Specification Core Specification 4.0 Core Specification 4.1 Bluetooth 4.1 FAQ Core Specification 4.2 Bluetooth 4.2 FAQ Core Specification 5.0 Core Specification 5.1 Core Specification 5.2 Core Specification 5.3 Core Specification 5.4 Core Specification 6.0 Core Specification 6.1 Core Specification 6.2 Core Specification 6.3 RF Switch Comparison Absorptive/Reflective Standards Comparison ETSI / FCC / ARIB requirements BLE Channel Sounding  - Overview BLE Channel Sounding - RF Hardware BLE Channel Sounding - ANSYS Modeling Tools  BLE Channel Sounding - Antenna Prototypes Validation Measurements Equipment Wireless Equipment: This article provides the links to the Equipment that helps to the project development  Useful Links How to import and run demo examples with MCUXpresso for Visual Studio Code: This article gives information on how to import and run demo examples from the new SDK with ARM GCC toolchain, in MCUXpresso for Visual Studio Code. [MCUXSDK] How to use GitHub SDK for KW4x, MCXW7x, MCXW2x - NXP Community this community post provides step by step how to use GitHub SDK [MCUXSDK] GitHub SDK - Documentation for Bluetooth LE platforms - NXP Community this community post provides the documentation for BLE platforms.  How to use the HCI_bb on Kinetis family products and get access to the DTM mode:  This article is presenting two parts: How to flash the HCI_bb binary into the Kinetis product. Perform RF measurement using the R&S CMW270 BLE HCI Application to set transmitter/receiver test commands: This article provides the steps to show how user could send serial commands to the device. Bluetooth LE HCI Black Box Quick Start Guide: This article describes a simple process for enabling the user controls the radio through serial commands.
View full article
    As the support for MCUXpresso IDE as GUI and toolchain will be stopped and will be replaced by MCUXpresso for Visual Studio Code, I am sharing here some essential steps to start development on Visual Studio Code and MCUXpresso plugin. Preparation: - MCUXpresso for VS Code is installed as an extension inside Microsoft VS Code - see https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-for-visual-studio-code:MCUXPRESSO-VSC - The rest of the toolchain including ARMGCC, west and other tools which work with MCUX for VS Code installation is available via MCUXpresso SDK option of the MCUXpresso Installer: https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-installer:MCUXPRESSO-INSTALLER - See also generic Getting Started Guide for MCUX SDK with MCUX for VS Code at: https://mcuxpresso.nxp.com/mcuxsdk/latest/html/gsd/run_a_demo_using_mcuxvsc.html   Here I will provide the procedure to import the loc_reader example from the repository.   Import the repository: The recommended approach is to import REMOTE ARCHIVE which has a similar environment as the legacy MCUXpresso IDE. Here I will provide the procedure to import the loc_reader example from the repository From the MCUXpresso plugin, select "Import Repository", then in the "REMOTE ARCHIVE" tab, select the board, the SDK version and the location: Wait for the repository to be imported, this procedure can take several minutes. Once the import is succeed, it will appear here: Import demo projects and run: Once the repository is successfully imported, you can then import demo examples from the repo by selecting "Import Example from Repository": then select the demo example from "Template". "AppType" should be "Freestanding application" if you want a standalone project. "Location" is where the project will be located.  "Toolchain" should be the Arm GNU one that you installed in preparation steps Build and run the imported project:  
View full article
Hello, all, Bellow you can find the necessary steps to enable dual monitor mode on our Wi-Fi chip: 88W9098. This procedure is helpful for using 88W9098's dual interfaces in monitor mode to simultaneously capture Wi-Fi sniffer logs in different band . Below is my test environment: Hardware: I.MX8MQ-EVK M.2 AzureWave PCIe XM458 module Software: Linux kernel version: L6.6.52 (prebuilt image for I.MX8MQ-EVK) Device Tree: imx8mq-evk-pcie1-m2.dtb Wi-Fi/BT Driver & Firmware: Version: PCIE9098--17.92.1.p149.81-MM6X17540.p33-(FP92) Firmware: nxp/pcieuart9098_combo_v1.bin Configuration: Edit wifi_mod_para.conf and add: mon_filter=0x27 max_vir_bss=2 Example configuration: PCIE9098_0 = { cfg80211_wext=0xf max_vir_bss=2 cal_data_cfg=none ps_mode=1 auto_ds=1 host_mlme=1 mon_filter=0x27 fw_name=nxp/pcieuart9098_combo_v1.bin } PCIE9098_1 = { cfg80211_wext=0xf max_vir_bss=2 cal_data_cfg=none ps_mode=1 auto_ds=1 host_mlme=1 mon_filter=0x27 fw_name=nxp/pcieuart9098_combo_v1.bin } Compile tcpdump Compile libpcap: wget https://www.tcpdump.org/release/libpcap-1.10.4.tar.gz tar -xvf libpcap-1.10.4.tar.gz cd libpcap-1.10.4 ./configure --host=arm-linux-gnueabihf --prefix=/opt/tcpdump make Output: libpcap.so.1.10.4 Compile tcpdump: wget https://www.tcpdump.org/release/tcpdump-4.99.4.tar.gz tar -xvf tcpdump-4.99.4.tar.gz cd tcpdump-4.99.4/ ./configure --host=arm-linux-gnueabihf --prefix=/opt/tcpdump --with-pcap=/opt/tcpdump make Output: tcpdump Deploy to Board: Copy libpcap.so.1.10.4 and tcpdump to the board Add execute permission: chmod +x tcpdump Dual Monitor Mode on 88W9098 Load the Wi-Fi drivers and firmware: modprobe moal mod_para=nxp/wifi_mod_para.conf Monitor Interface Setup 5 GHz (mlan0): iw mlan0 interface add mon0 type monitor ip link set mon0 up ip link set mlan0 down iw mon0 set channel 36 ./tcpdump -i mon0 -w capture_5g.pcap & ./tcpdump -r capture_5g.pcap 2.4 GHz (mmlan0): iw mmlan0 interface add mon1 type monitor ip link set mon1 up ip link set mmlan0 down iw mon1 set channel 6 ./tcpdump -i mon1 -w capture_2g.pcap & ./tcpdump -r capture_2g.pcap Simultaneous Capture ./tcpdump -i mon0 -w capture_5g.pcap & ./tcpdump -i mon1 -w capture_2g.pcap & Stop Capture killall tcpdump Read Captures ./tcpdump -r capture_5g.pcap ./tcpdump -r capture_2g.pcap Reference link: https://docs.nxp.com/bundle/RM00297/page/connectivity-features/topics/monitor_mode.html   Best regards, Christine.
View full article
In daily work, many customers are asking how to develop Mifare Desfire EV3. Yes, it is true that the Mifare Desfire EV3 is a highly secure product, and the related application documents are complicated and difficult for customers to use or take too much time to research, so I want to share them with you.
View full article
This article shares 2 step by step methods to create P2P connections between 2 IW612 modules. One is not setting pin code, another is setting pin code. And also shares local test results and printed logs for your reference. The basic environment: Hardware: 2 IW612 modules(Murata LBES5PL2EL) + I.MX93-EVK Software: Linux 6.12.20 Wi-Fi Driver and FW version = SDIW612---w9177o-V1, SDIO, FP99, 18.99.3.p25.7-MM6X18537.p9-GPL-(FP92) As a reference, you can also test on other NXP's Wi-Fi products based on Linux OS.   Best regards, Christine.
View full article
The slides were prepared for European School of Antennas at Carlos III University in Madrid. The contents: - About NXP and wireless controllers - About channel sounding and NXP solutions - Design of CS antennas and functional tests - CS antenna arrays and CS localization
View full article
Matter is the industry-unifying standard from the Connectivity Standards Alliance that is delivering reliable, secure and interoperable connectivity for smart home devices, ensuring that they will work seamlessly together, today and tomorrow. From connectivity to security, processing and software, NXP offers complete end-to-end solutions for accelerating the development of Matter-enabled devices and is focused on helping our customers overcome the complexity and challenges that come with developing around this game-changing technology.   Getting Started Our investment in Matter starts with easing the development experience for adopting Matter in existing or new designs. With the breadth and scale of our portfolios, we scale to the system level to enable the autonomous edge - bringing intelligence to the edge. This approach provides developers with integrated platforms for the processing, connectivity and security requirements to go from prototype to production faster.   Matter Open-Source Protocol Compatible Products    Matter (previously known as Project CHIP) is a single, unified, application-layer connectivity standard designed to enable developers to connect and build reliable, secure IoT ecosystems and increase compatibility among Smart Home and Building devices. Backed by major brands and developed through collaboration within the Connectivity Standards Alliance (previously known as the Zigbee Alliance), Matter is an open-source royalty-free connectivity standard built with market-proven technologies using Internet Protocol (IP) and compatible with Thread and Wi-Fi network transports.   Useful Links   Getting Started with MCUXpresso for VS Code: Matter on Windows (24.12.71) MCUXpresso extension for VS Code v24.12.71 integrates the Matter toolchain for development on Windows, macOS and Linux.    Understanding Matter Terminology   Matter Is What's Cooking and NXP Has All the Right Ingredients     Matter GitHub Links    Releases Matter 
View full article
NXP wireless solutions build upon decades of Wi-Fi, Bluetooth®, multiprotocol silicon, software and system design expertise, including 802.15.4 in the latest tri-radio architectures. NXP is committed to driving large-scale deployment across multiple markets by a broad array of power- and cost-optimized Wi-Fi, Bluetooth and 802.15.4 transceivers, enabling products with advanced Wi-Fi and multiradio capabilities including Wi-Fi 4, Wi-Fi 5 and Wi-Fi 6 chips.   Market Product Wi-Fi Spec Wi-Fi Support Summary  IoT IW623 802.11ax (Wi-Fi 6E) 2x2 Tri-band (2.4G/5/7 GHz) + 1x1 Single Band (2.4 GHz) supports Wi-Fi 6E, with a high-performance 2x2 tri-band module for fast and flexible connectivity, plus an extra 1x1 2.4 GHz module likely for compatibility or low-power tasks IoT IW693 802.11ax (Wi-Fi 6/6E) CDW 2x2 Dual Band (5-7 GHz) + 1x1 Single Band (2.4 GHz) High-speed, low-latency connectivity on modern bands (5 and 6 GHz). Compatibility with older devices via 2.4 GHz A 2x2 MIMO setup for better performance, plus a 1x1 fallback for basic connections IoT IW610 802.11ax (Wi-Fi 6) 1x1 DB (2.4/5 GHz)   IoT IW612 802.11ax (Wi-Fi 6) 1x1 DB (2.4/5 GHz)   IoT IW611 802.11ax (Wi-Fi 6) 1x1 DB (2.4/5 GHz)   IoT IW620 802.11ax (Wi-Fi 6) 2x2 DB (2.4/5 GHz)   IoT IW416 802.11n (Wi-Fi 4) 1x1 DB (2.4/5 GHz)       Markets Product Wi-Fi Spec Wi-Fi Support Summary Wireless MCU Hostless RW612 802.11ax (Wi-Fi 6) 1x1 DB (2.4/5 GHz) supports Wi-Fi 6, has a single antenna (1x1), and can connect to both 2.4 GHz and 5 GHz networks. Wireless MCU Hostless RW610 802.11ax (Wi-Fi 6) 1x1 DB (2.4/5 GHz) supports Wi-Fi 6, has a single antenna (1x1), and can connect to both 2.4 GHz and 5 GHz networks.   Markets Product Wi-Fi Spec Wi-Fi Support Automotive AW692 802.11ax (Wi-Fi 6) 2x2 + 1x1 CDW DB (2.4/5GHz + 2.4Ghz) Automotive AW693 802.11ax (Wi-Fi 6E) 2x2 + 1x1 CDW TB (2.4/5/6Ghz + 2.4Ghz) Automotive AW611 802.11ax (Wi-Fi 6) 1x1 DB (2.4/5 GHz) Automotive AW690 802.11ax (Wi-Fi 6) 1x1 CDW DB (2.4/5 GHz)   Wireless Module Partners Leading wireless connectivity solution providers offer NXP wireless modules in their wireless connectivity solutions. Module manufacturers develop Wi-Fi modules using NXP’s broad portfolio of Wi-Fi chips (system-on-chip (SoC)), including Wi-Fi 6 chips, Wi-Fi and Bluetooth® combo integrated circuits (ICs) and tri-radio SoCs with 802.15.4. NXP enables a broad range of wireless applications with an ecosystem of wireless module partners.   Why Use a Module Vendor? Accelerate time-to-market Avoid the complexity of RF design and testing Ensure regulatory compliance more easily (e.g. FCC, CE, ISED) Focus on the host product’s functionality while relying on the vendor for wireless performance   Useful Links Wi-Fi Basic concepts: This post provides information about the different terms used in Wi-Fi, 802.11 standards and the three types of 802.11 MAC frames. Wi-Fi Security Concepts: This post covers the security and authentication processes  Wi-Fi Connection/Disconnection process: In 802.11 standards, the connection procedure includes three major steps that shall be performed to make the device part of the Wi-Fi network and communicate in the network. Wi-Fi Software Drivers Locations: NXP Recommends using Wi-Fi source code drivers WiFi_BT_Integretation-(Linux_BSP_compilation_for_iMX_platform): This article describes how to compile the Linux BSP of the i.MX platform under ubuntu 18.04, 20.04 LTS and debian-10. This is a necessary step to integrate WIFI/BT to the I.MX platform. See the attachment for detailed steps. Enabling i.MX8MP-EVK uSDHC1 M.2 for Wi-Fi on Android-11.0.0_2.6.0: Detailed steps on enabling usdhc1 NXP Wi-Fi and Bluetooth Product:  The article will introduce how to build Wi-Fi Mass Market Driver Wi-Fi Firmware Automatic Recovery on RW61x: This article introduces the Wi-Fi automatic recovery feature as well as how to enable and verify it on RW61x SDK. Access Point Wi-Fi configuration on i.MX8 Family: This guide explains how to achieve that, using the i.MX8M Plus EVK (8MP) as the AP device and the i.MX8M Mini EVK (8MM) as the connected device. How to connect to a Wi-Fi network on i.MX8MP: this article guides you step by step how to connect to a Wi-Fi network NXP Wi-Fi/Bluetooth firmware on the i.MX8M series: steps to replace Wi-Fi/Bluetooth firmware on the i.MX8M series on Linux Enabling Wi-Fi on Zephyr projects with the FRDM-RW612: In this guide, we'll modify the mqtt_publisher example—originally designed for Ethernet—to work with Wi-Fi instead Training FRDM-iMX91 connectivity Wi-Fi Basic Hands-on FRDM-iMX91 connectivity Wi-Fi Bluetooth LE and OT COEX RW612/MCXW71 - Wi-Fi and thread border router Training FRDM-RW612 Getting Started, Wi-Fi CLI on VScode Community Support If you have questions regarding this training, please leave your comments in our Wireless MCU Community! here 
View full article
In modern embedded systems, precise and reliable clocking is fundamental to the correct operation of digital peripherals. Microcontrollers like NXP’s KW45 and MCXW71 rely on internal oscillators to provide timing references for peripherals such as UART, SPI, timers, and ADCs. One such oscillator is the 6 MHz Free Running Oscillator (FRO6M), which is commonly used as a default clock source. This article provides a comprehensive guide to: Selecting and configuring alternative clock sources Choosing an alternative clock source The KW45/MCXW71 microcontroller offers several alternatives, including the Free Running Osilator 192Mhz (FRO192), the RF_OSC , and external crystal oscillators. Each option has its own advantages: FRO192 is stable and available, and external oscillators provide long-term accuracy. The choice of clock source should be based on the peripheral’s timing requirements, power constraints, and the availability of the clock in the current operating mode. Reconfiguring Peripheral Clock Sources Reconfiguring a peripheral’s clock source in KW45 is straightforward using the SDK’s clock management APIs. The function CLOCK_SetIpSrc() allows developers to assign a new clock source to a specific peripheral. Example on changing a UART clocking from FRO6M to other clocksource. UART peripheral connected to FRO6M   uint32_t uartClkSrcFreq = BOARD_DEBUG_UART_CLK_FREQ; CLOCK_SetIpSrc(kCLOCK_Lpuart1, kCLOCK_IpSrcFro6M); DbgConsole_Init(BOARD_DEBUG_UART_INSTANCE, BOARD_DEBUG_UART_BAUDRATE, BOARD_DEBUG_UART_TYPE, uartClkSrcFreq);   For example, to switch a UART from FRO6M to FRO-192M, the following code can be used: //Replace kCLOCK_Lpuart1 for your peripheral for clicking CLOCK_SetIpSrc(kCLOCK_Lpuart1, kCLOCK_IpSrcFro192M); Also in the example above we would have to set the  uint32_t uartClkSrcFreq  variable to the correct freq value corresponding to the FRO192M as it is being used as clock source, but the same logic applies to any other clock source for the peripheral.   Other clocking changes for modules can be done as shown in this examples: //Change clock source for LPIT 0 module from 6M FRO to other clocksources /* Iniital source for the LPIT module */ CLOCK_SetIpSrc(kCLOCK_Lpit0, kCLOCK_IpSrcFro6M); /* Set the new source for the LPIT 0 module */ CLOCK_SetIpSrc(kCLOCK_Lpit0, kCLOCK_IpSrcFro192M); /* Set the corresponding divider for application, need to be decided by developer*/ CLOCK_SetIpSrcDiv(kCLOCK_Lpit0, 15U); /* Set the source for the TPM 0 module */ CLOCK_SetIpSrc(kCLOCK_Tpm0, kCLOCK_IpSrcFro6M); /* Set the source for the TPM 0 module */ CLOCK_SetIpSrc(kCLOCK_Tpm0, kCLOCK_IpSrcFro192M); /* Set the corresponding divider for application, need to be decided by developer*/ CLOCK_SetIpSrcDiv(kCLOCK_Tpm0, 3U); //Change clock source for Luart 1 module from 6M FRO to other clocksources CLOCK_SetIpSrc(kCLOCK_Lpuart1, kCLOCK_IpSrcFro6M); /* Set the source for the Lpuart 1 module */ CLOCK_SetIpSrc(kCLOCK_Lpuart1, kCLOCK_IpSrcFro192M); uartClkSrcFreq = CLOCK_GetIpFreq(kCLOCK_Lpuart1); DbgConsole_Init(BOARD_DEBUG_UART_INSTANCE, BOARD_DEBUG_UART_BAUDRATE, BOARD_DEBUG_UART_TYPE, uartClkSrcFreq); After changing the clock source, it is important to reinitialize the peripheral to ensure that timing parameters such as baud rate, prescaler, or sampling intervals are correctly recalculated. This step ensures that the peripheral operates reliably with the new clock configuration. Those were some examples on changing clock sources for some peripherals, but the same logic can be applied to any other module or peripheral, those examples were taken from SDK 2.16.00 as an example on how a module configured with a clock source can be switched to another.
View full article
See the necessary steps to enable additional SDK components for a project when using GitHub SDK and Kconfig/CMake.
View full article
Board pictures (KW47-M2) Connectors (KW47-M2) Part Identifier Connector Type Description J3 2x5 pin header SWD DNP J8 1x6 pin header UART1 – FTDI DNP J9 1x6 pin header Power connector DNP Jumpers (KW47-M2) Part Identifier Connector Type Description JP5 2x3 pin header supply power source selection jumper: 1-2 shorted (default configuration): Use this configuration to set target MCU in DCDC mode.  3-4 shorted: Use this configuration to set target MCU in LDO/Bypass mode. All MCU power domains are supplied by P3V3_DUT.  JP4 1x2 pin header Target MCU boot configuration enable jumper: • Open (default setting): ISP mode is disabled • Shorted: ISP mode is enabled Push Buttons (KW47-M2) Part Identifier Switch name Description SW1 Reset button Resets the target MCU. This causes peripherals to reset to their default state. After this, MCU ROM bootloader will be executed. LED D1 turns on at SW1 press. SW2 User PB General purpose input. This pin supports low-power wakeup capabilities through Wake-Up Unit (WUU). LEDs (KW47-M2) Part Identifier Switch name Description D1 Reset LED Indicates a system reset event. When reset is triggered—such as by pressing the SW1 reset button—the D1 LED turns ON. D2 Led Green User indicator, indicates system activity   Power Configurations (KW47-M2) Populate J9 PWR connector. To run KW47 M2 as standalone, supply 3.3V to P3V3_DUT power rail Figure 1 J9 M10 Configuration (KW47-M2)   To get the KW47 M2 up and running, you need to select a power configuration through JP5 jumper. For more information on KW47 power configurations, refer to RM: Part Identifier pin Description JP5 1-2 1-2 shorted (default setting): Sets target MCU to DCDC mode. This mode is the recommended configuration. JP5 3-4 3-4 shorted: Sets target MCU to LDO mode.     External power configuration (KW47-M2) Enable KW47-M2 by supplying power through J9 connector: Note: When using DCDC or LDO mode, it is recommended to supply P3V3_DUT power rail only. Part Identifier pin Description J9 5 Use this pin to supply P3V3_DUT power rail with 3.3V. To get KW47-M2 up and running, it is recommended to set KW47 to DCDC mode and supply P3V3_DUT only. J9 3 Use this pin to supply P1V8_LDO power rail with 1.8V. This power rail is intended for an accurate control of VDD_RF power domain, but it is not necessary. J9 1 Use this pin to supply P1V1_EXT power rail with 1.1V. This power rail is intended for an accurate control of VDD_CORE power domain, but it is not necessary.     Programming the NBU in the KW47-M2 board The following steps guide you to program the NBU software for the KW47-M2 Place a jumper on the JP4 header while holding down the reset button (SW) on the module board. Then, connect the USB cable to the J8 connector (USB-to-serial bridge) and plug it into your computer. After the USB cable is connected, release the reset button.   Verify what COM Port was assigned to your KW47-M2 board. You can check the COM Port assigned in the Windows “Device Manager” program. Search for “Ports (COM & LPT)” and save the COM Port number. In this example the COM Port assigned was “COM19”   Navigate to your computer to the MCU-Link installation folder. The default installation path is located at “C:\nxp\LinkServer_25.3.31\MCU-LINK_installer Locate the “bin” folder and open it. Run the script “blhost” within a windows command prompt.   Type “blhost.exe -p COMX write-memory 0x48800000”, drag and drop the NBU binary file. When the process is ready you will see the response status "success"  
View full article
Hello, Starting with SDK version 24.12.00, documentation is available online at: https://mcuxpresso.nxp.com/mcuxsdk/latest/html/index.html  To view documentation for previous releases, replace latest in the URL with the specific version number: - example: https://mcuxpresso.nxp.com/mcuxsdk/25.03.00/html/index.html    Bluetooth LE Documentation For Bluetooth LE-related resources, refer to the following sections:  Bluetooth LE Host Documentation (change log and guides): https://mcuxpresso.nxp.com/mcuxsdk/latest/html/middleware/wireless/bluetooth/index.html    Connectivity Framework Documentation(change log and guides):  https://mcuxpresso.nxp.com/mcuxsdk/latest/html/middleware/wireless/framework/index.html   Release Notes by platform To view what's new for each platform, refer to the "What is new" section in the respective release notes: KW45 - EVK:  https://mcuxpresso.nxp.com/mcuxsdk/latest/html/boards/Wireless/kw45b41zevk/releaseNotes/rnindex.html   KW47-EVK:  https://mcuxpresso.nxp.com/mcuxsdk/latest/html/boards/Wireless/kw47evk/releaseNotes/rnindex.html FRDM-MCXW23:  https://mcuxpresso.nxp.com/mcuxsdk/latest/html/boards/MCX/frdmmcxw23/releaseNotes/rnindex.html  Regards, Ovidiu    
View full article
Hello,  Here are some helpful steps to follow when working with the NXP GitHub SDK. Step1: Ensure the necessary toolchains are installed:  https://mcuxpresso.nxp.com/mcuxsdk/latest/html/gsd/repo.html  Additional notes and links: VS code: https://code.visualstudio.com/ MCUXpresso plugin: https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-for-visual-studio-code:MCUXPRESSO-VSC Getting started with MCUXpresso for VS Code: https://www.nxp.com/design/design-center/training/TIP-GETTING-STARTED-WITH-MCUXPRESSO-FOR-VS-CODE   Step 2: Download and Install the SDK: GUI Method: - Open VS Code, navigate to Import Repository and select the Remote option as shown below: - Upon successful import, the repository will show up in the Imported Repositories window:    Command Line Method: - west commands: # Initialize west with the manifest repository west init -m https://github.com/nxp-mcuxpresso/mcuxsdk-manifests/ mcuxpresso-sdk # Update the west projects cd mcuxpresso-sdk west update More details:  https://mcuxpresso.nxp.com/mcuxsdk/latest/html/gsd/installation.html#get-mcuxpresso-sdk-repo  - import the local repository to VS code: Open VS Code, navigate to Import Repository and select the Local option and Browse.. to your local repo:   Step3: Run a Bluetooth LE Example Step3a: Run a Bluetooth LE Example using MCUXpresso for VS code - click Import Example from Repository from the QuickStart Panel - From the open dialog, select the MCUXpresso SDK, the Arm GNU toolchain, your target board, desired template, and application type, and proceed by clicking Import:   For the application type, you’ll typically see two options:  - Repository application  - Freestanding application. The key difference lies in where the project is imported. Repository applications are placed within the MCUXpresso SDK directory, while Freestanding applications can be imported to a custom location defined by the user. - Next, VS Code will prompt you to verify trust for the imported files—click Yes. Navigate to the PROJECTS view. - Identify your project, right click and select the Prestine Build icon to begin building:  - details of the build are into the terminal window: - using Debug button will allow you to download and debug the software:   (useful link: https://mcuxpresso.nxp.com/mcuxsdk/latest/html/gsd/run_a_demo_using_mcuxvsc.html ) Step3b: Run a Bluetooth LE Example using IAR Embedded Workbench for ARM: - use the west list_projects command to list the supported example for boards and the corresponding toolchain: Example to list Bluetooth examples:  west list_project -p .\examples\wireless_examples\bluetooth\ or if you know the platform or/and the project you can use: west list_project -b kw45b41zevk -p .\examples\wireless_examples\bluetooth\w_uart  west list_project -b frdmmcxw23 -p .\examples\wireless_examples\bluetooth\w_uart   Once you've confirmed that the project is available for the IAR toolchain, run the appropriate command to build it: west build -p always examples/wireless_examples/bluetooth/w_uart/freertos --toolchain iar --config debug -b kw45b41zevk The build folder will contain the generated output:   To work with IDE add  -t guiproject in the west command: west build -p always examples/wireless_examples/bluetooth/w_uart/freertos --toolchain iar --config debug -b kw45b41zevk -t guiproject --pristine --build-dir=build/w_uart_freertos_kw45    The result of the build will indicate the path to the *.eww/*.ewp:   (additional details: https://mcuxpresso.nxp.com/mcuxsdk/latest/html/gsd/run_project.html )   Step4: Create a standalone example With the freestanding project approach, only the application code is included in the export folder. Other essential files remain linked to the repository. To generate a complete standalone project, the recommended method is using West by adding -t standalone_project option. Example of command for kw45b41zevk, IAR toolchain: west build -b kw45b41zevk ./examples/wireless_examples/bluetooth/w_uart/freertos -p always --toolchain iar --config debug -t standalone_project -d c:\work\w_uart_kw45  The result of the build will indicate the path to the *.eww/*.ewp:   Example of command for kw45b41zevk, armgcc toolchain: west build -b kw45b41zevk ./examples/wireless_examples/bluetooth/w_uart/freertos -p always --toolchain armgcc --config debug -t standalone_project -d c:\work\w_uart_KW45_armgcc The result of the build will indicate the path to the project that need to be imported in VsCode: Regards, Ovidiu  
View full article
Useful Links: Bluetooth Ranging Access Vehicle Enablement System - NXP Community
View full article
Blue Ravens (Bluetooth Ranging Access Vehicle Enablement System) is a system solution developed by NXP to assist customers in designing their own BLE-based car access solutions using NXP products. It is designed to support a variety of car access use cases through a modular approach. The main objective (but not limited) is to present all the capabilities and advantages of the Channel Sounding technology and NXP BLE Handover in an automotive use case. Channel Sounding is part of the new Bluetooth Low Energy (BLE) standard (BLE 6.0) as a highly accurate distance measurement solution, and available on the NXP KW47 chip. BLE Handover is an NXP proprietary feature developed by NXP to seamlessly transfer a BLE connection from one device to another, without disconnection, using and out of band channel (e.g. CAN). This transfer does not impact the peer device so interoperability is guaranteed. This feature can also be used to enable BLE connection RSSI sniffing to increase RSSI based system security. (KW45 & KW47) Thanks to its modularity, this system can be used to address multiple use-cases, from simple BLE connection system, up to a full BLE Channel Sounding positioning system. Please, note that Channel Sounding is only supported on KW47 chip. KW45 can only be used for simple BLE system. By default, the system on KW47 covers a basic use of Channel Sounding to measure the distance between one remote device (Digital Key) and alternatively several different fixed devices (Car Anchor). At each instant in time, only one anchor is connected to the Digital Key. The other anchors (not connected) can be set in Connection RSSI Sniffing mode (based on Handover). This mode increase the system security by accessing the RSSI value of a connection instead of an advertising packet. These RSSI values can be used to estimated which anchor can be used in the round-robin or to keep the best BLE link around the Car.     The system is composed of multiple KW4x boards, each with a specific role. On board is used as Digital Key, to be caried by the user, the other represent the Car sub-system. On this Car Sub-system, all boards are connected to each other using the CAN bus. The CAN bus fulfills the purpose to power all boards with 12V and to allow communication between the boards: Control Unit (KW4x EVK-Board) Car Anchors (KW4x LOC-Board) Digital Key (KW4x LOC-Board) Role: Central decision-making node Functionality: - Coordinates BLE anchors. - Triggers actions based on received data   Role: BLE devices connected to the Control Unit via CAN bus Functionality: - Advertise BLE presence. - Wait for a Digital Key to connect. - Act as CS initiators during the session. Role: Acts as the remote BLE device Functionality: - Scans for BLE anchors. - Initiates connection with a Car Anchor. - Once connected, behaves as a CS reflector.     A Desktop application is used to monitor the states and monitor the measurement done by the system:   Using the successive measurement on each anchors, the Car sub-system is able to estimate the Digital Key position (Disclaimer: this solution is not consider accurate in dynamic environments)       Features   BLE connection Supporting 1 connection only for now (multiple peer plan) BLE Channel Sounding (KW47 only) Yes RSSI Sniffing Yes – All not connected anchors Automatic exclusion of suboptimal anchors Yes BLE Handover with CS context (No CS repeat) Yes Trilateration algorithm Yes Measurement filtering (real time) Yes Detection area triggering action (e.g. Welcome zone) Yes Car Anchor CAN Synchronization (radio core sync) No (planned for next release) Channel Sounding Sniffing No (feasibility study ongoing)   KPIs   Number of Anchor From 2 to 8 Number of Digital Key 1 BLE Connection Interval 7.5ms – 4s (Default = 30ms) BLE Handover connection transfer time (+CS context transfer) <60ms (CI=30ms) <50ms (CI=10ms) CS start Delay (2+7)*CI CS measurement and data transfer (Real Time) <70ms (CI=30ms) CS Algo <30ms Full cycle time (CS + Handover) [Algorithm runs asynchronously on the anchor after the handover is finished] 390ms (CI=30ms) 190ms (CI=10ms) Line Of Sight CS measurement range 100m Max (at 10dBm) Back Pocket CS measurement range 10m (at 10dB)   This solution is under development and improvement will be added in the future releases. This system can also be enhanced with Ultra-Wide Band support. Videos For access, please contact [email protected]  
View full article
As documented in the MCX W23 [ERRATA] for WLCSP packaged devices, Tx modulation quality can potentially be violated on 2 data channels
View full article
This article introduces the Wi-Fi automatic recovery feature as well as how to enable and verify it on RW61x SDK. 1. Introduction Wi-Fi automatic recovery is a NXP proprietary feature that monitors Wi-Fi running status and recovers Wi-Fi out of exception state when running into one of the following cases: Driver fails to wakeup Wi-Fi MCU for commands/Tx Driver fails to receive command response from Wi-Fi MCU Driver detects Wi-Fi firmware is in abnormal state Once Wi-Fi automatic recovery is triggered, Wi-Fi middleware and driver will clean up the running states, reset Wi-Fi MCU power, reload Wi-Fi firmware and restart Wi-Fi initialization. It will not impact the ongoing Bluetooth LE/802.15.4 activities. Figure 1 is the Wi-Fi software architecture. Figure 1: Wi-Fi Software Architecture Figure 2 shows the work flow of Wi-Fi automatic recovery: Figure 2: Wi-Fi Automatic Recovery Work Flow Wi-Fi driver detects command timeout/wakeup card timeout/FW exception   Wi-Fi driver triggers WLAN reset to Stop Wi-Fi activities and de-initialize Wi-Fi Reset Wi-Fi power Reload the Wi-Fi only firmware and wait for the firmware to be active Send an event to notify the application before resetting it   2. SDK Configuration The Wi-Fi automatic recovery feature is not enabled by default in RW61x SDK. It needs to be enabled explicitly: Add below line in <example>/source/wifi_config.h to enable the feature  #define CONFIG_WIFI_RECOVERY 1 Besides, please also make sure the "CONFIG_WIFI_RESET" macro is defined as "1" in the SDK.   3. Automatic Recovery Verification This section introduces how to verify the Wi-Fi automatic recovery feature on RW61x SDK. wifi_cli application is used as example here together with the RW612 RD board. Refer to UM11799: NXP Wi-Fi and Bluetooth Demo Applications for RW61x for steps to flash and run Wi-Fi applications. Below are the steps to verify the Wi-Fi automatic recovery feature: Step 1: Define CONFIG_WIFI_RECOVERY in wifi_cli/source/wifi_config.h     #define CONFIG_WIFI_RECOVERY 1 Step 2: Build and flash the wifi_cli application onto RW612 RD board Step 3: Connect RW612 RD board to a serial terminal Step 4: Reset the power of RW612 RD board Step 5: Trigger Wi-Fi MCU into hung-up state with the following command to mimic a command timeout     # wlan-recovery-test Step 6: Wi-Fi recovery background task detects Wi-Fi FW hang and starts recovery process [wifi] Warn: Command response timed out. command 0x8b, len 12, seqno 0x1c timeout happends. # app_cb: WLAN: FW hang Event: 14 --- Disable WiFi --- [wifi] Warn: Recovery in progress. command 0x10 skipped [wifi] Warn: Recovery in progress. command 0x10 skipped [wifi] Warn: Recovery in progress. command 0xaa skipped [dhcp] Warn: server not dhcpd_running. --- Enable WiFi --- Initialize WLAN Driver [wifi] Warn: WiFi recovery mode done! Wi-Fi cau temperature : 31 STA MAC Address: C0:95:DA:01:1D:A6 board_type: 2, board_type mapping: 0----QFN 1----CSP 2----BGA app_cb: WLAN initialized ======================================== WLAN CLIs are initialized ======================================== ENHANCED WLAN CLIs are initialized ======================================== HOST SLEEP CLIs are initialized ======================================== CLIs Available: ======================================== help clear wlan-version wlan-mac wlan-thread-info wlan-net-stats wlan-set-mac <MAC_Address> wlan-scan wlan-scan-opt ssid <ssid> bssid ... wlan-add <profile_name> ssid <ssid> bssid... wlan-remove <profile_name> wlan-list wlan-connect <profile_name> wlan-connect-opt <profile_name> ... wlan-reassociate wlan-start-network <profile_name> wlan-stop-network wlan-disconnect wlan-stat wlan-info wlan-address wlan-uap-disconnect-sta <mac address> wlan-get-uap-channel wlan-get-uap-sta-list wlan-ieee-ps <0/1> wlan-set-ps-cfg <null_pkt_interval> wlan-deep-sleep-ps <0/1> wlan-get-beacon-interval wlan-get-ps-cfg wlan-set-max-clients-count <max clients count> wlan-get-max-clients-count wlan-rts <sta/uap> <rts threshold> wlan-frag <sta/uap> <fragment threshold> wlan-host-11k-enable <0/1> wlan-host-11k-neighbor-req [ssid <ssid>] wlan-host-11v-bss-trans-query <0..16> wlan-mbo-enable <0/1> wlan-mbo-nonprefer-ch <ch0> <Preference0: 0/1/255> <ch1> <Preference1: 0/1/255> wlan-get-log <sta/uap> <ext> wlan-roaming <0/1> <rssi_threshold> wlan-multi-mef <ping/arp/multicast/del> [<action>] wlan-wakeup-condition <mef/wowlan wake_up_conds> wlan-auto-host-sleep <enable> <mode> <rtc_timer> <periodic> wlan-send-hostcmd wlan-ext-coex-uwb wlan-set-uap-hidden-ssid <0/1/2> wlan-eu-crypto-rc4 <EncDec> wlan-eu-crypto-aes-wrap <EncDec> wlan-eu-crypto-aes-ecb <EncDec> wlan-eu-crypto-ccmp-128 <EncDec> wlan-eu-crypto-ccmp-256 <EncDec> wlan-eu-crypto-gcmp-128 <EncDec> wlan-eu-crypto-gcmp-256 <EncDec> wlan-set-antcfg <ant_mode> <evaluate_time> <evaluate_mode> wlan-get-antcfg wlan-scan-channel-gap <channel_gap_value> wlan-wmm-stat <bss_type> wlan-reset wlan-set-regioncode <region-code> wlan-get-regioncode wlan-11d-enable <sta/uap> <0/1> wlan-uap-set-ecsa-cfg <block_tx> <oper_class> <new_channel> <switch_count> <bandwidth> wlan-csi-cfg wlan-set-csi-param-header <sta/uap> <csi_enable> <head_id> <tail_id> <chip_id> <band_config> <channel> <csi_monitor_enable> <ra4us> wlan-set-csi-filter <opt> <macaddr> <pkt_type> <type> <flag> wlan-txrx-histogram <action> <enable> wlan-subscribe-event <action> <type> <value> <freq> wlan-reg-access <type> <offset> [value] wlan-uapsd-enable <uapsd_enable> wlan-uapsd-qosinfo <qos_info> wlan-uapsd-sleep-period <sleep_period> wlan-tx-ampdu-prot-mode <mode> wlan-rssi-low-threshold <threshold_value> wlan-rx-abort-cfg wlan-set-rx-abort-cfg-ext enable <enable> margin <margin> ceil <ceil_thresh> floor <floor_thresh> wlan-get-rx-abort-cfg-ext wlan-cck-desense-cfg wlan-net-monitor-cfg wlan-set-monitor-filter <opt> <macaddr> wlan-set-monitor-param <action> <monitor_activity> <filter_flags> <radio_type> <chan_number> wlan-set-tsp-cfg <enable> <backoff> <highThreshold> <lowThreshold> <dutycycstep> <dutycycmin> <highthrtemp> <lowthrtemp> wlan-get-tsp-cfg wlan-get-signal wlan-set-bandcfg wlan-get-bandcfg wlan-set-ips <option> wlan-enable-disable-htc <option> wlan-set-su <0/1> wlan-set-forceRTS <0/1> wlan-set-mmsf <enable> <Density> <MMSF> wlan-get-mmsf wlan-set-multiple-dtim <value> wlan-set-country <country_code_str> wlan-set-country-ie-ignore <0/1> wlan-single-ant-duty-cycle <enable/disable> [<Ieee154Duration> <TotalDuration>] wlan-dual-ant-duty-cycle <enable/disable> [<Ieee154Duration> <TotalDuration> <Ieee154FarRangeDuration>] wlan-external-coex-pta enable <PTA/WCI-2/WCI-2 GPIO> ExtWifiBtArb <enable/disable> PolGrantPin <high/low> PriPtaInt <enable/disable> StateFromPta <state pin/ priority pin/ state input disable> SampTiming <Sample timing> InfoSampTiming <Sample timing> TrafficPrio <enable/disable> CoexHwIntWic <enable/disable> wlan-sta-inactivityto <n> <m> <l> [k] [j] wlan-get-temperature wlan-auto-null-tx <sta/uap> <start/stop> wlan-detect-ant <detect_mode> <ant_port_count> channel <channel> ... wlan-recovery-test wlan-get-channel-load <set/get> <duration> wlan-get-txpwrlimit <subband> wlan-set-chanlist wlan-get-chanlist wlan-set-txratecfg <sta/uap> <format> <index> <nss> <rate_setting> <autoTx_set> wlan-get-txratecfg <sta/uap> wlan-get-data-rate <sta/uap> wlan-get-pmfcfg wlan-uap-get-pmfcfg wlan-set-ed-mac-mode <interface> <ed_ctrl_2g> <ed_offset_2g> <ed_ctrl_5g> <ed_offset_5g> wlan-get-ed-mac-mode <interface> wlan-set-tx-omi <interface> <tx-omi> <tx-option> <num_data_pkts> wlan-set-toltime <value> wlan-set-rutxpwrlimit wlan-11ax-cfg <11ax_cfg> wlan-11ax-bcast-twt <dump/set/done> [<param_id> <param_data>] wlan-11ax-twt-setup <dump/set/done> [<param_id> <param_data>] wlan-11ax-twt-teardown <dump/set/done> [<param_id> <param_data>] wlan-11ax-twt-report wlan-get-tsfinfo <format-type> wlan-set-clocksync <mode> <role> <gpio_pin> <gpio_level> <pulse width> wlan-suspend <power mode> ping [-s <packet_size>] [-c <packet_count>] [-W <timeout in sec>] <ipv4/ipv6 address> iperf [-s|-c <host>|-a|-h] [options] dhcp-stat ======================================== --- Done --- Step 7: Run other Wi-Fi shell commands to confirm Wi-Fi resumes to normal state  
View full article
Introduction: Bluetooth Low Energy offers the ability to broadcast data in format of non-connectable advertising packets while not being in a connection. This GAP Advertisement is widely known as a beacon.   In this post we will explore some of the features of the beacon_freertos example included in the SDK package of the KW45B41Z Evaluation Kit for MCUXpresso, for updating a counter every 5 seconds and broadcasting its value with the beacon, so the user can see it using the IoT Toolbox application.    Setup: 1 – SDK installation Download the latest version of the KW45B41Z-EVK SDK package from MCUXpresso SDK Builder Drag and drop the SDK zip file into the Installed SDKs window:   2 – Importing the project In the QuickStart Panel, click on Import SDK example From wireless_examples, select beacon_freertos. It is recommended to select UART for Debug Console when using BLE projects.  Click on finish   App Customization  1 – app_preinclude.h file: Set the following definitions to "0" in order to disable Extended Advertising and Low Power functionality.   2 – app_advertiser.h file: Add these aux prototypes that will allow to get and set the value of some flags.   /*Functions for data exchanging with beacon application*/ bool_t GetBleAppStarted(void); bool_t GetmAdvertisingOn(void); void SetmAdvertisingOn(bool_t value);   3 – app_advertiser.c file: Include fsl_component_timer_manager.h Add the macro UPDATE_BEACON_TIMER (5) to set the update timer to 5 seconds Create a timer ID by using TIMER_MANAGER_HANDLE_DEFINE Declare the callback for the timer Declare and define the "flag" BleAppStarted Include extern variable gAppAdvertisingData   Define the aux functions that will allow to get and set the value of BleAppStarted and mAdvertisingOn flags.   Define the timer callback, which will add the value of the counter into "A" field of the Beacon packet. #include "fsl_component_timer_manager.h" #define UPDATE_BEACON_TIMER (5) //in seconds /*Create timer ID*/ static TIMER_MANAGER_HANDLE_DEFINE(BeaconUpdateDataTimerID); /*Callback prototype*/ static void UpdateBeaconTimerCallback(void * pParam); /*Define the variables*/ static bool_t BleAppStarted = FALSE; static bool_t mAdvertisingOn = FALSE; /*Declare variable as external*/ extern gapAdvertisingData_t gAppAdvertisingData; /*Define functions for data echange*/ bool_t GetBleAppStarted(void) { return BleAppStarted; } bool_t GetmAdvertisingOn(void) { return mAdvertisingOn; } void SetmAdvertisingOn(bool_t value) { mAdvertisingOn = value; } /*define the timer callback*/ static void UpdateBeaconTimerCallback(void * pParam) { /*Value that will be advertised*/ static int32_t count = 1; /* Stop ADV and handle the update on the callbacks*/ Gap_StopAdvertising(); mAdvertisingOn = !mAdvertisingOn; /* On ADV data 0-1 = company ID, 2 = Beacon ID, 3 -18 = UUID, /* 19-20: A Data, 21-22: B Data, 23-24: C Data */ gAppAdvertisingData.aAdStructures[1].aData[19] = (uint8_t)((count >> 8) & 0xFF); gAppAdvertisingData.aAdStructures[1].aData[20] = (uint8_t)(count & 0xFF); count++; }   Inside App_AdvertiserHandler function, gAdvertisingParametersSetupComplete_c event is triggered when the advertising parameters setup is complete. Here, Advertising Data is set, and we are going to use this event to start the timer. Once the Advertising Data Setup is complete, we are going to use gAdvertisingDataSetupComplete_c event in App_AdvertiserHandler function to start advertising and update the timer. Every time the Data Setup is complete, the timer will start again.  case gAdvertisingParametersSetupComplete_c: { (void)Gap_SetAdvertisingData(mpAdvParams->pGapAdvData, mpAdvParams->pScanResponseData); if (!BleAppStarted) { BleAppStarted = TRUE; /*Allocate timer*/ (void) TM_Open(BeaconUpdateDataTimerID); /* Start data update timer */ (void) TM_InstallCallback((timer_handle_t) BeaconUpdateDataTimerID, UpdateBeaconTimerCallback, NULL); (void) TM_Start((timer_handle_t) BeaconUpdateDataTimerID, (uint8_t) kTimerModeSingleShot | (uint8_t) kTimerModeLowPowerTimer, TmSecondsToMilliseconds(UPDATE_BEACON_TIMER)); } } break; case gAdvertisingDataSetupComplete_c: { (void) Gap_StartAdvertising(App_AdvertisingCallback, App_ConnectionCallback); /* Start data update timer */ (void) TM_InstallCallback((timer_handle_t) BeaconUpdateDataTimerID, UpdateBeaconTimerCallback, NULL); (void) TM_Start((timer_handle_t) BeaconUpdateDataTimerID, (uint8_t) kTimerModeSingleShot | (uint8_t) kTimerModeLowPowerTimer, TmSecondsToMilliseconds(UPDATE_BEACON_TIMER)); } break;   4 – beacon.c file:  Wrap the mAppExtAdvParams structure inside gBeaconAE_c definition macro to avoid problems with the declaration of the extended advertising parameters  #if defined(gBeaconAE_c) && (gBeaconAE_c) static appExtAdvertisingParams_t mAppExtAdvParams = { &gExtAdvParams, &gAppExtAdvertisingData, NULL, mBeaconExtHandleId_c, gBleExtAdvNoDuration_c, gBleExtAdvNoMaxEvents_c }; #endif /*gBeaconAE_c */   BleApp_AdvertisingCallback handles BLE Advertising callback from the host stack. Every time advertising state changes, we are going to update Advertising Data when the device is not advertising and BleApp has already started. Replace the existing content of gAdvertisingStateChanged_c event.  case gAdvertisingStateChanged_c: { /* update ADV data when is disabled */ if((!GetmAdvertisingOn()) && GetBleAppStarted()) { Gap_SetAdvertisingData(&gAppAdvertisingData, NULL); SetmAdvertisingOn(true); } if(GetmAdvertisingOn()) { Led1On(); } else { Led1Off(); #if defined(gBeaconAE_c) && (gBeaconAE_c) if(mAppTargetState == mAppState_ExtAdv_c) { if (gBleSuccess_c != BluetoothLEHost_StartExtAdvertising(&mAppExtAdvParams, BleApp_AdvertisingCallback, NULL)) { panic(0, 0, 0, 0); } } #endif } } break;   Testing the application: The IoT Toolbox is an all-in-one application that demonstrates NXP’s BLE functionalities, the implementation of BLE and custom profiles and the compatibility with different smartphones. This mobile application can be downloaded from the App Store and Google Play Store.  Please, refer to the IoT Toolbox Mobile Application User Manual for more information on features, requirements and how to install the application.  Select Beacons  Press scan Press the USERINTERFACE Button (carrier board) to start advertising  In the IoT Toolbox app, you should be able to see the counter increasing its value every 5 seconds in the field "A"
View full article
Using the Signal Frequency Analyzer (SFA) to Measure the FRO 6M Frequency Overview The Signal Frequency Analyzer (SFA) is a specialized hardware peripheral available in NXP’s KW45, MCXW71 microcontrollers. It is designed to provide precise, real-time measurement and analysis of digital signal characteristics, including frequency, period, and timing intervals. This makes it a valuable tool for applications requiring accurate timing diagnostics, signal validation, and system debugging. By utilizing internal 32-bit counters and configurable trigger mechanisms, the SFA enables high-resolution capture of signal transitions, supporting robust system monitoring and fault detection. Functional Capabilities of the SFA The SFA module supports the following measurements: Clock signal frequency of a Clock Under Test (CUT) Clock signal period It operates using two 32-bit counters: One for the Reference Clock (REF) One for the Clock Under Test (CUT) Measurement is performed by comparing the counts of both clocks until predefined target values are reached. FRO 6M Frequency Failure Scenarios The 6 MHz Free Running Oscillator (FRO6M) may occasionally output an incorrect frequency under certain conditions: When the device exits reset When the device wakes from low-power modes To mitigate potential issues caused by incorrect FRO6M output, it is the application developer’s responsibility to verify the oscillator’s frequency and apply corrective measures as needed. Monitoring the FRO 6M Using the SFA To monitor the FRO6M signal, the following configuration is recommended: SFA Configuration Parameters Reference Clock (REF): CPU Clock (e.g., 96 MHz) Clock Under Test (CUT): FRO6M routed via CLKOUT Interrupt Mode: Enabled for asynchronous measurement completion Code Implementation The presented functions are meant to be implemented in users application, the inner functions are part of the implementations of the SFA driver from the NXP’s SDK. It can be used on MCXW71, KW45 just make sure SFA Peripheral Initialization  void init_SFA_peripheral(void) { /* Enable SFA interrupt. */ EnableIRQ(SFA_IRQn); /* Set SFA interrupt priority. */ NVIC_SetPriority(SFA_IRQn, 1); SFA_Init(DEMO_SFA_BASEADDR); SFA_InstallCallback(DEMO_SFA_BASEADDR, EXAMPLE_SFA_CALLBACK); } SFA Callback Function void EXAMPLE_SFA_CALLBACK(status_t status) { if (status == kStatus_SFA_MeasurementCompleted) { SfaMeasureFinished = true; } sfa_callback_status = status; } Frequency Measurement Function This function sets up the measurement of the FRO6M signal using the CPU clock as the reference. uint8_t SFA_freq_measurement_6M_FRO(void) { uint8_t ratio = 0; uint32_t freq = 0UL; sfa_config_t config; CLOCK_SetClkOutSel(kClockClkoutSelSirc); //set clokout to SIRC SFA_GetDefaultConfig(&config); //Get SFA default config config.mode = kSFA_FrequencyMeasurement0; config.refSelect = kSFA_REFSelect1; //Set CPU clk as ref clk config.cutSelect = kSFA_CUTSelect1; //Set clkout as CUT config.refTarget = 0xFFFFFFUL; config.cutTarget = 0xFFFFUL; config.enableCUTPin = true; freq = get_ref_freq_value(CPU_CLK); SFA_SetMeasureConfig(DEMO_SFA_BASEADDR, &config); SFA_MeasureNonBlocking(DEMO_SFA_BASEADDR); while (1) { if (SfaMeasureFinished) { SfaMeasureFinished = false; if(kStatus_SFA_MeasurementCompleted == sfa_callback_status) { freq = SFA_CalculateFrequencyOrPeriod(DEMO_SFA_BASEADDR, freq);//Calculate the FRO freq if(FREQ_6MHZ + TOLERANCE <= freq ) { ratio = 1; } else { if(FREQ_3MHZ + TOLERANCE <= freq) { ratio = 2; } else { if(FREQ_2MHZ + TOLERANCE <= freq) { ratio = 3; } else { ratio = 4; } } } break; } } else { __WFI(); } } return ratio; } Result Interpretation and Usage To test the FRO 6M after adding the above functions the FRO can be tested after executing: init_SFA_peripheral(); SFA_freq_measurement_6M_FRO(); The measured FRO6M frequency ratio is returned by the function SFA_freq_measurement_6M_FRO(), with the ratio you can know the current frequency output of the 6M FRO, ration 1 means 6M are being output by the FRO, ratio 2 means the frequency output of the FRO it's being cut in half meaning the FRO is outputting 3 Mhz, ration 3 means the FRO output frequency is being cut by a third part, this results in 2MHz frequency output. With this information you can: Adapt peripheral clocking if the FRO6M frequency is incorrect (This can be achieve by modifying the peripheral dividers if dividers are being used). Trigger corrective actions such as  switching to an alternate clock source Steps to Reconfigure Peripheral Clocking When FRO6M output frequency is lower Detect the Faulty FRO6M Output Use the SFA measurement as described earlier to determine if the FRO6M is operating below its expected frequency (6 MHz). If the result is significantly lower, proceed to reconfigure. Choose an Alternative Clock Source Most NXP MCUs offer multiple internal and external clock sources. Common alternatives include: FRO 192M OSC RF 32M Sys OSC RTC OSC Choose one that is: Stable Available in your current power mode Compatible with the peripheral’s timing requirements You can add more clock divers if needed to make a higher frequency clock reach a certain lower frequency. Reconfigure the Peripheral Clock Source Use the SDK’s CLOCK_Set... APIs to change the clock source. You may also need to: Adjust dividers to match the required baud rate or timing Reinitialize the peripheral with the new clock settings Example Scenario: Measuring the FRO and Adjusting UART Based on Frequency Ratio Imagine your application relies on the 6 MHz Free Running Oscillator (FRO), and its accuracy directly affects UART communication. To ensure reliable operation, you can use the System Frequency Adjustment (SFA) feature to monitor the FRO output and dynamically adjust the UART configuration. After measuring the 6 MHz FRO using the recommended method, the system returns a frequency ratio value. This value ranges from 1 to 4, where: 1 indicates the frequency is within expected limits (no issues), 2 to 4 represent varying degrees of deviation from the expected frequency. Using this ratio, you can initialize and configure the UART peripheral and its driver to compensate for any frequency variation, ensuring stable and accurate communication. */ int main(void) { BOARD_InitHardware(); uint8_t ch = 0; uint8_t FRO_ratio = 0; init_SFA_peripheral(); /*Measure FRO6M output frequency*/ FRO_ratio = SFA_freq_measurment_6M_FRO(); /*Init debug console and compensate in case a different frequency is output */ if(0 == FRO_ratio) { assert(0);//this user defined return value means something went wrong while measuring 6Mz FRO } uint32_t uartClkSrcFreq = BOARD_DEBUG_UART_CLK_FREQ/FRO_ratio;//Compensate the src frequency set for uart module CLOCK_EnableClock(kCLOCK_Lpuart1); CLOCK_SetIpSrc(kCLOCK_Lpuart1, kCLOCK_IpSrcFro6M); DbgConsole_Init(BOARD_DEBUG_UART_INSTANCE, BOARD_DEBUG_UART_BAUDRATE, BOARD_DEBUG_UART_TYPE, uartClkSrcFreq); ...... } SDK 25.0.00 Enhancements for FRO6M Calibration To address known reliability issues with the 6 MHz Free Running Oscillator (FRO6M), particularly during transitions from low-power modes, SDK version 25.06.00 introduces a set of software enhancements aimed at improving oscillator validation and calibration. Key Features Introduced FRO6M Calibration API Two new functions have been added to facilitate runtime verification of the FRO6M frequency: PLATFORM_StartFro6MCalibration() Initializes the calibration process by enabling the cycle counter, capturing a timestamp, and preparing the system to measure elapsed time using both the CPU and the FRO6M-based timestamp counter. PLATFORM_EndFro6MCalibration() Completes the calibration by comparing the time measured via CPU cycles and the FRO6M timestamp counter. This comparison determines whether the oscillator is operating at the expected 6 MHz or has erroneously locked to a lower frequency (e.g., 2 MHz). The result is stored in a global ratio variable (fwk_platform_FRO6MHz_ratio) for use by the system. These functions provide a lightweight and efficient mechanism to detect and respond to oscillator misbehavior, ensuring system stability and timing accuracy. Configuration Macro gPlatformEnableFro6MCalLowpower_d This macro enables automatic FRO6M frequency verification upon exiting low-power modes. When defined, the system will invoke the calibration functions to validate the oscillator before resuming normal operation. Default Integration The calibration mechanism is enabled by default in the SDK configuration file fwk_config.h, ensuring that all applications benefit from this safeguard without requiring manual setup. Use Case and Benefits These enhancements are particularly valuable in applications where: Precise timing is critical (e.g., wireless communication, sensor sampling). The system frequently enters and exits low-power states. Clock source integrity must be guaranteed to avoid peripheral misbehavior or timing faults. By integrating these calibration routines, developers can proactively detect and correct FRO6M frequency anomalies, improving overall system robustness and reducing the risk of runtime errors due to clock instability.  
View full article