RF_ON Issue on PN5180

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RF_ON Issue on PN5180

RF_ON Issue on PN5180

The customer submitted a case through DFAE to seek support from NXP. They designed
the product using PN5180, and according to feedback, about 10% of the boards could
not read the card. The specific manifestation of the problem is: after the host issues the
RF_ON command, RF field seems cannot be turned on and then fails to detect the card.
Therefore, it can be seen that the problem should be on TX, not RX. The customer's
device does not enable DPC and LPCD.

附件
无评分
版本历史
最后更新:
‎04-28-2025 07:49 PM
更新人: