ワイヤレス接続に関するナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wireless Connectivity Knowledge Base

ディスカッション

ソート順:
This document describes the Persistent Data Manager (PDM) module which handles the storage of stack context data and application data in Non-Volatile Memory (NVM). For the KW41Z devices, this memory is internal Flash and this document will therefore refer to Flash. Tip: In this document, a cold start refers to either a first-time start or a re-start without memory (RAM) held. A warm start refers to a re-start with memory held (for example following sleep with memory held). 1.    Overview If the data needed for the operation of a network node is stored only in on-chip RAM, this data is maintained in memory only while the node is powered and will be lost during an interruption to the power supply (e.g. power failure or battery replacement). This data includes context data for the network stack and application data. In order for the node to recover from a power interruption with continuity of service, provision must be made for storing essential operational data in Non-Volatile Memory (NVM), such as Flash. This data can then be recovered during a re-boot following power loss, allowing the node to resume its role in the network. The storage and recovery of operational data in KW41Z Flash can be handled using the Persistent Data Manager (PDM) module, as described in the rest of this document, which covers the following topics: Initializing the PDM module - see Section 2 Managing data in Flash - see Section 3 PDM features like record searching by record ID – see Section 4 The PDM can be used with ZigBee PRO and IEEE802.15.4 wireless networking protocols. 2.    Initializing the PDM and Building a File System Using the Kinetis NVM framework requires that the user must register the necessary data sets for NVM writing. This is done by calling function NVM_RegisterDataSet(). This function registers the given data set to be written in the NVM_TABLE section from Flash. The PDM module must be initialized by the application following a cold or warm start, irrespective of the PDM functionality used (e.g. context data storage or counter implementation). PDM initialization is performed using the function PDM_eInitialise(). This function requires the following information to be specified: The number of Flash sectors to be used by PDM (a zero value means use all segments) Once the PDM_eInitialise() function has been called, the PDM module builds a file system in RAM containing information about the sectors that it manages in Flash. The PDM reads the header data from each Flash sector and builds the file system. Application records are grouped and initialized in function InitAplRecords(), while network stack records are grouped and initialized in function InitNwkRecords(). For ZigBee PRO, the PDM is used in its most general form, as described above. 3.    Managing Data in Flash This section describes use of the PDM module to persist data in Flash in order to provide continuity of service when the KW41Z device resumes operation after a cold start or a warm start without memory held. Data is stored in Flash in terms of ‘records’. A record occupies at least one Flash sector but may be larger than a sector and occupy multiple sectors. Any number of records of different lengths can be created, provided that they do not exceed the Flash capacity. The records are created automatically for stack context data and by the application (as indicated in Section 3.1) for application data. Each record is identified by a unique 16-bit value which is assigned when the record is created - for application data, this identifier is user-defined. The stack context data which is stored in Flash includes the following: Application layer data: AIB members, such as the EPID and ZDO state Group Address table Binding table Application key-pair descriptor Trust Centre device table Network layer data: NIB members, such as PAN ID and radio channel Neighbor table Network keys Address Map table On performing a KW41Z cold start or warm start without RAM held, the PDM must be initialized in the application as described in Section 2. If this is the first ever cold start, there will be no stack context data or application data preserved in the Flash. If it is a cold or warm start following previous use (such as after a reset), there should be stack context data and application data preserved in the Flash. On start-up, the PDM builds a file system in RAM and scans the Flash for valid data. If any data is found, it is incorporated in the file system. Saving and recovering application data in Flash are described in the subsections below. 3.1   Saving Data to Flash       Application data and stack context data are saved from RAM to Flash as described below.       Note: During a data save, if the Flash needs to be defragmented and purged, this will be performed automatically resulting in all records being re-saved.     Application data           You should save application data to Flash when important changes have been made to the data in RAM. Application data in RAM can be saved to an individual record           in Flash using the function PDM_eSaveRecordData(). A buffer of data in RAM is saved to a single record in Flash (a record may span multiple Flash sectors).          The records are created when calling PDM_eInitialise(). These records are traced by a unique 16-bit identifier assigned by the application - this identifier is subsequently          used to reference the record. The value used must not clash with those used by the NXP libraries - the ZigBee PRO stack libraries use values above 0x8000.          Subsequently, in performing a re-save to the same record (specified by its 16-bit identifier), the original Flash sectors associated with the record will be overwritten but          only the sector(s) containing data changes will be altered (if no data has changed, no write will be performed). This method of only making incremental saves improves          the occupancy level of the size-restricted Flash.     Stack Context Data          The NXP ZigBee PRO stack automatically saves its own context data from RAM to Flash when certain data items change. This data will not be encrypted. 3.2   Recovering Data from Flash       Application data and stack context data are loaded from the Flash to RAM as described below.     Application Data             During a cold start or a warm start without memory held, once the PDM module has been initialized (see Section 2.2), PDM_eReadDataFromRecord() must be called             for each record of application data in Flash that needs to be copied to RAM.     Stack Context Data             The function PDM_eReadDataFromRecord(), described above, is not used for records of stack context data. Loading this data from the Flash to RAM is handled             automatically by the stack (provided that the PDM has been initialized). 3.3   Deleting Data in Flash         All records (application data and stack context data) in the Flash can be deleted using the function PDM_vDeleteAllDataRecords().          Caution: You are not recommended to delete records of ZigBee PRO stack context data by calling PDM_vDeleteAllDataRecords() before a rejoin of the same secured          network. If these records are deleted, data sent by the node after the rejoin will be rejected by the destination node since the frame counter has been reset on the source          node. For more information and advice, refer to the “Application Design Notes” appendix in the ZigBee 3.0 Stack User Guide. 4.    PDM Features PDM offers a function that can be used to search for a specific record by using the 16-bit record ID. This function is called PDM_GetNVMTableEntry() and the required parameters are the record ID and an output pointer for the found entry. Another available PDM feature is providing a mechanism to safely write the data to NVM. This is done by calling the function PDM_vCompletePendingOperations(), which calls the appropriate NVM function that is used to complete all writings to NVM before any other operation. As an example, user can use this function to make sure that the data is written to the NVM before a reset.
記事全体を表示
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-340508
記事全体を表示
QTool is a PC software tool that works with QN9080 USB dongle to assist in the development of BLE projects with the QN9080. You control the dongle via the QTool software, which issues and receives FSCI (Framework Serial Communication Interface) formatted commands over a virtual COM port. The dongle can then act either as a master or a slave to a QN9080DK board over BLE.  Before using the BLE dongle with QTool though, the firmware on the QN9080 Dongle must be updated. The updated firmware can be found inside the QTool installation directory, and you will need to put the dongle into bootloader mode to drag-and-drop new firmware on it. Updating the Firmware on the QN9080 Dongle. 1. Install QTool: https://www.nxp.com/webapp/sps/download/license.jsp?colCode=Connectivity-QTool-Setup   2. Plug the QN9080 Dongle into a USB port on your computer 3. Using a wire, connect TP5 to ground. You can use either TP4 or the USB shield for GND. 4. While that wire is connected, press the reset button on the dongle. This will now put the dongle into bootloader mode. 5. A drive will enumerate on your computer named “CRP_DISABLD”     6. You can now remove the wire 7. Delete the firmware.bin file found in that drive 8. Drag-and-drop the firmware.bin file found in C:\NXP\Connectivity QTool\bin files into that enumerated drive. 9. Once done copying, unplug and replug in the USB Dongle, and the new firmware will now be running.  Installing the QN9080 Dongle Driver The dongle will enumerate as a USB CDC COM device. If the CDC driver is not automatically detected, you will need to manually install the driver. 1. Right-click Computer and choose Properties, the System Management window appears. 2. Click Device Manager and navigate to MCU VIRTUAL COM DEMO      3. Right-click the device MCU VIRTUAL COM DEMO and choose Update Driver Software 4. Click the  Browse my computer for driver software option in the window. 5. Click Browse button to go to the folder  C:\NXP\Connectivity QTool\drivers 6. Click the Next button at the bottom to install the driver.  7. After the driver is installed you will see the Virtual Com Port device under the Ports category    Using QTool: Now that the QN9080 dongle has the updated firmware and has the correct driver installed, you can follow the instructions in the QTool documentation found at C:\NXP\Connectivity QTool\UM11085.pdf Related documentation: QN908x Quick Start Guide QN908x DK User's Guide
記事全体を表示
FRDM-KW36 Software Development Kit (SDK) includes drivers and examples of FlexCAN module for KW36 which can be easily configured for a custom communication. For example, if user want to change the default baud rate from FlexCAN driver demo examples then the only needed change is the default value on "config->baudRate" and "config->baudRateFD" from "FLEXCAN_GetDefaultConfig" function (See Figure 1). Segments within a bit time will be automatically configured to obtain the desired baud rate. By default, demos are configured to work with CAN FD communication. Figure 1. FRDM-KW36's default baudrate from flexcan_interrupt_transfer driver example Even so, there are cases where segments within a bit time are not well configured and it's necessary that user configure segments manually. An example occurs by setting the maximum FD baud rate "3.2MHz" using the 32MHz xtal or "2.6MHz" using a 26MHz xtal where demo reports an error. See Figure 2. Figure 2. Error by setting maximum baud rate When this error occurs, the fix is on setting the timing config parameters correctly by including the definition of SET_CAN_QUANTUM on application source file (see Figure 3) and then declare and initialize the timing config parameters shown in Figure 4. Figure 3. SET_CAN_QUANTUM define Figure 4. Custom timing config parameters For this example we are going to show how to calculate timing config parameters in an scenario where a CAN FD communication is used with baud rate of 500kHz on nominal phase and 3.2MHz on FD phase. See Figure 5.  To do it, we need to calculate Time Quanta and value of segments within the bit time.    Figure 5. Custom CAN FD baudrate KW36 Reference Manual in chapter "37.4.8.7 Protocol timing" shows the segments within a bit time for CAN nominal phase configured in "CAN_CTRL1" register (see Figure 6), and segments for FD phase configured in CAN_FDCBT register (see Figure 7). Figure 6. Segment within a bit time for CAN nominal phase Figure 7. Segment within a bit time for CAN FD phase Before calculating the value of segments, first we need to calculate the Time Quanta which is the atomic number of time handled by the CAN engine. The formula to calculate Time Quanta is shown in Figure 8 taken from KW36 Reference Manual. Figure 8. Time Quanta Formula CANCLK can be selected by CLKSRC bits on CAN_CTRL1 register as shown in Figure 9, where the options are Peripheral clock=20MHz or Oscillator clock (16MHz if using 32MHz xtal or 13MHz if using 26MHz xtal). The recomiendation is to use the Oscillator clock due to peripheral clock can have jitter that affect communication.  Figure 9. CAN clocks To select the Oscillator clock, search for flexcanConfig.clkSrc definition and set it to kFLEXCAN_ClkSrcOsc as shown in Figure 10. Figure 10. CANCLK selection Next step is selecting the PRESDIV value for nominal phase and FPRESDIV for FD phase. You have to select the right value to achieve the TQ needed to obtain the configured baudrate. For this example, let's set FPRESDIV value to 0 and PRESDIV value to 3. TQ calculation for nominal phase: TQ = (PRESDIV + 1) / CANCLK = (3 + 1) / 16000000 = 0.00000025 TQ calculation for FD phase: TQ = (FPRESDIV + 1) / CANCLK = (0 + 1) / 16000000 = 0.0000000625 The bit rate, which defines the rate of CAN message is given by formula shown in Figure 11 taken from KW36 Reference Manual. Figure 11. CAN Bit Time and Bit Rate Formulas With this info and with our TQ calculated, we can deduce that we need: For Nominal phase: 8 = Number of Time Quanta in 1 bit time For FD phase: 5 = Number of Time Quanta in 1 bit time Now, let's define the value of segments. For nominal phase: Bit Time =  (number of Tq in 1 bit time) x Tq CAN Bit Time = (1 + (PROPSEG + PSEG1 + 2) + (PSEG2 + 1) ) x Tq CAN Bit Time = (1 + (1 + 2  + 2) + (1 + 1) ) x Tq = 8 x 0.00000025 =  Baud rate = 1/ CAN Bit Time = 500KHz For FD phase: CAN Bit Time = (number of Tq in 1 bit time) x Tq CAN Bit Time = (1 + (FPROPSEG + FPSEG1 + 1) + (FPSEG2 + 1) ) x Tq CAN Bit Time = (1 + (0 + 1 + 1) + (1 + 1) ) x Tq = 5 x Tq =  0.0000003125 Bit Rate = 1/CAN Bit Time = 1 / 0.0000003125 =  3.2MHz To finish, just update the calculated values on your firmware on flexcanConfig.timingConfig structure.  Notes: FRDM-KW36 Software Development Kit (SDK) can be downloaded from MCUXpresso webpage. FlexCAN driver examples are located in path: "SDK_2.2.0_FRDM-KW36\boards\frdmkw36\driver_examples" from your downloaded FRDM-KW36 SDK. Take in consideration that not all the baud rates are achievables and will depend on the flexcan clock and segment values used.
記事全体を表示
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-332703
記事全体を表示
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-340993
記事全体を表示
When having several ZigBee Networks in the same area, and therefore several potential parents, it may become necessary to join one of them and discard the rest. While having a mechanism to only accept joining devices when desired is the best method (like using a button to trigger the joining), it might not always be possible since the parent nodes could be commercial devices or another vendor’s product without this feature. Below are some mechanisms that could be used for this purpose. In general, when searching for suitable parents, the process is as follows: ZDO of device to join sends a MAC scan request. The MAC layer starts scan. For every beacon it receives, it sends a beacon notify indication that is processed in ParseBeaconNotifincaiton() function from AppStackImpl.c The ParseBeaconNotifincaiton() function will add the relevant information in the discovery table and for this it needs a free entry, so it calls GetFreeEntryInDiscoveryTable() function with reuse parameter as FALSE. If the table is full, it will call GetFreeEntryInDiscoveryTable() with reuse set to TRUE to literally re-use low priority entries. When the MAC scan has finished, it will send a MAC scan confirm. When this reaches ZDO, the SearchForSuitableParent() function is called. At this point, there are several approaches that could be used: Use a specific Extended PAN ID to search only for a specific parent node Use a specific PAN ID to prioritize the network’s ID Search in a specific Channel where network is supposed to be operating in All these parameters are configurable in ApplicationConf.h file of the project’s Configure Folder and used in SearchForSuitableParent() function to filter Discovery table entries. Nevertheless, those solutions are not always the best for all applications since it may require hard-coding the network’s parameters. Fortunately, BeeStack leaves all this open for any modification in case it is necessary. In brief, if the discovery table gets full with suitable parents that you DO NOT want to use, you should update the "if(reuse)" statement of the GetFreeEntryInDiscoveryTable() function to replace an entry. In other words, if you think that the desired parent is not present in the discovery table (due to its size limitation or other reason), you should update the GetFreeEntryInDiscoveryTable() function to make sure discovery table contains only devices that are of interest to your node. Please note that the criteria used to select the desired parents is totally application specific. As mentioned, it is always best having a way to trigger the joining such as a button so the rest of parents have permit join set to FALSE and therefore join only to the desired parent without having to implement custom code. Anyway, you may select the solution that meets your application’s requirements the most.
記事全体を表示
Introduction This post guides you on migrating from MKW36Z512VHT4 to MKW36A512VFT4 MCUs. This example will make use of the "beacon" SDK example. SDK Download and Install 1- Go to MCUXpresso web page: MCUXpresso Web Page 2- Log in with your registered account. 3- Search for the "KW36A" device. Then click on the suggested processor and click on "Build MCUXpresso SDK"       4- The next page will be displayed. Select “All toolchains” in the “Toolchain / IDE” box and provide a name to identify the package. Then click on "Download SDK".     5- Accept the license agreement. Wait a few minutes until the system gets the package into your profile. Download the SDK clicking on "Download SDK Archive" as depicted in the following figure.     6- If MCUXpresso IDE is used, drag and drop the KW36A SDK zip folder in “Installed SDK’s” perspective to install the package.     At this point, you have downloaded and installed the SDK package for the KW36A device.   Software Migration in MCUXpresso IDE 1- Import the "beacon" example on the MCUXpresso workspace. Click on “Import SDK examples(s)…” option, a new window will appear. Then select "MKW36Z512xxx4" and click on the FRDM-KW36 image. Click on the "Next >" button.     2- Search beacon and select your project version (bm or freertos).     3- Go to Project/Properties. Expand C/C++ Build/MCU settings and select MKW36A512xxx4 MCU. Click Apply and Close button to save the configuration.     4- Rename MKW36Z folders as MKW36A, clicking the right mouse button and selecting "Rename". These are the following:   framework/DCDC/Interface -> MKW36Z framework/DCDC/Source -> MKW36Z framework/LowPower/Interface -> MKW36Z framework/LowPower/Source -> MKW36Z framework/XCVR -> MKW36Z4     5- Open the Project/Properties window in MCUXpresso IDE. Go to C/C++ Build/Settings and select MCU C Compiler/Includes folder in the Tool Settings window. Edit all paths related to MKW36 MCU, in according to MKW35 folders before created. The results must look similar as shown below:   ../framework/LowPower/Interface/MKW36A ../framework/LowPower/Source/MKW36A ../framework/DCDC/Interface/MKW36A ../framework/XCVR/MKW36A4     6- Select MCU Assembler/General folder in Tool Settings. Edit the paths related to MKW36 MCU. The results must look similar as shown below:   ../framework/LowPower/Interface/MKW36A ../framework/LowPower/Source/MKW36A ../framework/DCDC/Interface/MKW36A ../framework/XCVR/MKW36A4     7- Go to Project/Properties. Expand MCU C Compiler/Preprocessor window. Edit "CPU_MKW36Z512VHT4" and "CPU_MKW36Z512VHT4_cm0plus" symbols, rename it as "CPU_MKW36A512VFT4" and "CPU_MKW36A512VFT4_cm0plus" respectively. Save the changes.     8- Go to the workspace. Delete “fsl_device_registers, MKW36Z4, MKW36Z4_features, system_MKW36Z4.h and system_MKW36Z4.c” files located at CMSIS folder. Then, unzip the MKW35Z SDK package and search for “fsl_device_registers, MKW36A4, MKW36A4_features, system_MKW36A4.h and system_MKW36A4.c” files into this folder at the following paths:   <SDK_folder_root>/devices/MKW36A4/fsl_device_registers.h <SDK_folder_root>/devices/MKW36A4/MKW36A4.h <SDK_folder_root>/devices/MKW36A4/MKW36A4_features.h <SDK_folder_root>/devices/MKW36A4/system_MKW36A4.h <SDK_folder_root>/devices/MKW36A4/system_MKW36A4.c     9- Overwirte the “startup_mkw36z4.c” (located inthe startup folder) by the "startup_mkw36a4.c" located in the following path <SDK_folder_root>/devices/MKW36A4/mcuxpresso/startup_mkw36a4.c. You can simply drag and drop on the startup folder, and remove the older one.     10- Open "fsl_device_registers.h" file in CMSIS folder. Add"defined(CPU_MKW36A512VFT4)" in the following code (line 18 of the file):   /* * Include the cpu specific register header files. * * The CPU macro should be declared in the project or makefile. */ #if (defined(CPU_MKW36A512VFP4) || defined(CPU_MKW36A512VFT4) || defined(CPU_MKW36A512VHT4) || defined(CPU_MKW36A512VFT4))‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   11- Open "ble_config.h" file in bluetooth->host->config folder. Add "defined(CPU_MKW36A512VFT4)" in the following code (line 146 of the file):   /* The maximum number of BLE connection supported by platform */ #if defined(CPU_QN9080C) #define MAX_PLATFORM_SUPPORTED_CONNECTIONS 16 #elif (defined(CPU_MKW36Z512VFP4) || defined(CPU_MKW36Z512VHT4) || defined(CPU_MKW36A512VFP4) || defined(CPU_MKW36A512VHT4) || defined(CPU_MKW36A512VFT4) || \ defined(CPU_MKW35Z512VHT4) || defined(CPU_MKW35A512VFP4) || \ defined(CPU_K32W032S1M2CAx_cm0plus) || defined(CPU_K32W032S1M2VPJ_cm0plus) || \ defined(CPU_K32W032S1M2CAx_cm4) || defined(CPU_K32W032S1M2VPJ_cm4) || \ defined(CPU_MKW38A512VFT4) || defined (CPU_MKW38Z512VFT4) || defined(CPU_MKW39A512VFT4) || \ defined(CPU_MKW37A512VFT4) || defined(CPU_MKW37Z512VFT4))‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   12- Open "ble_controller_task.c" file in source->common folder. Add "defined(CPU_MKW36A512VFT4)" in the following code (line 272 of the file):    #elif (defined(CPU_MKW35A512VFP4) || defined(CPU_MKW35Z512VHT4) || defined(CPU_MKW36A512VFP4) || defined(CPU_MKW36A512VFT4) ||\ defined(CPU_MKW36A512VHT4) || defined(CPU_MKW36Z512VFP4) || defined(CPU_MKW36Z512VHT4)) /* Select BLE protocol on RADIO0_IRQ */ XCVR_MISC->XCVR_CTRL = (uint32_t)((XCVR_MISC->XCVR_CTRL & (uint32_t)~(uint32_t)( XCVR_CTRL_XCVR_CTRL_RADIO0_IRQ_SEL_MASK )) | (uint32_t)( (0UL << XCVR_CTRL_XCVR_CTRL_RADIO0_IRQ_SEL_SHIFT) ));‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   13-Build the project.   At this point, the project is already migrated.   Software Migration in IAR Embedded Workbench IDE 1- Open the beacon project located in the following path: 2- Select the project in the workspace and press Alt + F7 to open project options.   3- In the General Options/Target window click the icon next to the device name and select the appropriate device NXP/KinetisKW/KW3x/NXP MKW36A512xxx4, then click the OK button.   4- Create a new folder with the name MKW36A at following paths: <SDK_root>/middleware/wireless/framework_5.4.6/DCDC/Interface <SDK_root>/middleware/wireless/framework_5.4.6/DCDC/Source <SDK_root>/middleware/wireless/framework_5.4.6/LowPower/Interface <SDK_root>/middleware/wireless/framework_5.4.6/LowPower/Source <SDK_root>/middleware/wireless/framework_5.4.6/XCVR     5- Copy all files inside MKW36Z folders located at the above paths and paste in MKW36A folders.     6- Select the beacon project in the workspace and press Alt+F7 to open project options window. In C/C++ Compiler/Preprocessor window, rename the paths related to MKW36Z folders to MKW36A folders. Rename the CPU_MKW36Z512VHT4 macro as CPU_MKW36A512VFT4 in the defined symbols text box. The results must look similar as shown below: Click the OK button. $PROJ_DIR$/middleware/wireless/framework_5.4.2/LowPower/Interface/MKW36A $PROJ_DIR$/../../../../../../../devices/MKW36A4/drivers $PROJ_DIR$/../../../../../../../middleware/wireless/framework_5.4.2/DCDC/Interface/MKW36A $PROJ_DIR$/../../../../../../../middleware/wireless/framework_5.4.2/XCVR/MKW36A4 $PROJ_DIR$/../../../../../../../devices/MKW36A4 $PROJ_DIR$/../../../../../../../devices/MKW36A4/utilities     7- Expand the startup folder, select all files, click the right mouse button and select the “Remove” option. Click the right mouse button on the folder and select “Add/Add files”. Add the startup_MKW36A4.s located at this path: <SDK_root>/devices/MKW36A4/iar/startup_MKW36A4.s Also, add system_MKW36A4.c and system_MKW36A4.h into the startup folder. Both files are located at the next path: <SDK_root>/devices/MKW36A4   8- Open "ble_config.h" file in bluetooth->host->config folder. Add "defined(CPU_MKW36A512VFT4)" in the following code: /* The maximum number of BLE connection supported by platform */ #if defined(CPU_QN9080C) #define MAX_PLATFORM_SUPPORTED_CONNECTIONS 16 #elif (defined(CPU_MKW36Z512VFP4) || defined(CPU_MKW36Z512VHT4) || defined(CPU_MKW36A512VFP4) || defined(CPU_MKW36A512VHT4) || defined(CPU_MKW36A512VFT4) || \ defined(CPU_MKW35Z512VHT4) || defined(CPU_MKW35A512VFP4) || \ defined(CPU_K32W032S1M2CAx_cm0plus) || defined(CPU_K32W032S1M2VPJ_cm0plus) || \ defined(CPU_K32W032S1M2CAx_cm4) || defined(CPU_K32W032S1M2VPJ_cm4) || \ defined(CPU_MKW38A512VFT4) || defined (CPU_MKW38Z512VFT4) || defined(CPU_MKW39A512VFT4) || \ defined(CPU_MKW37A512VFT4) || defined(CPU_MKW37Z512VFT4))‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   9- Open "ble_controller_task.c" file in source->common folder. Add "defined(CPU_MKW36A512VFT4)" in the following code: #elif (defined(CPU_MKW35A512VFP4) || defined(CPU_MKW35Z512VHT4) || defined(CPU_MKW36A512VFP4) || defined(CPU_MKW36A512VFT4) ||\ defined(CPU_MKW36A512VHT4) || defined(CPU_MKW36Z512VFP4) || defined(CPU_MKW36Z512VHT4)) /* Select BLE protocol on RADIO0_IRQ */ XCVR_MISC->XCVR_CTRL = (uint32_t)((XCVR_MISC->XCVR_CTRL & (uint32_t)~(uint32_t)( XCVR_CTRL_XCVR_CTRL_RADIO0_IRQ_SEL_MASK )) | (uint32_t)( (0UL << XCVR_CTRL_XCVR_CTRL_RADIO0_IRQ_SEL_SHIFT) ));‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   10-Build the project.   At this point, the project is already migrated.
記事全体を表示
The purpose of this document is to communicate known issues with the FRDM-KW41Z development platform.  This document applies to all revisions of the FRDM-KW41Z development platform.  However, items are divided among their respective revisions and each item may or may not apply to all revisions.  Revision A The known issues, which may cause confusion for new customers, for revision A are as follows: 1) Incorrect default jumper configuration Issue:  Jumper, J24, shunt connector does not shunt pins 1 and 2, as noted in the schematic notes.   Impact:  Customers will not, by default, be able to put the OpenSDA circuit into bootloader mode.   Workaround:  There is currently only one workaround for this issue. Move shunt connector on jumper, J24, to shunt pins 1 and 2.   2) Default OpenSDA application may lose serial data Issue:  In certain situations, the serial to USB bridge portion of the default OpenSDA application may not correctly forward serial data. This problem typically only occurs after a POR of a development platform.   Impact: Customers may experience data loss when using the serial to USB converter functionality in their application.  Workaround:  There is currently one workaround for this issue.   Update to the latest JLink OpenSDA firmware.  To update to this firmware, consult sections 2.1 and 2.2 of the OpenSDA User Guide (found here:  http://cache.freescale.com/files/32bit/doc/user_guide/OPENSDAUG.pdf ).  The latest JLink OpenSDA firmware can be found here:  SEGGER - The Embedded Experts - Downloads - J-Link / J-Trace .  (Note:  Be sure to select the correct development platform.)                                                             3) Unable to measure correct IDD current when operating in buck mode and P3V3_BRD is disconnected Issue:  When configured for buck mode operation and J8 does not have a shunt connector, it is expected that P3V3_BRD will not be powered and thus, board peripherals will not be powered (thermistor, I2C line pull-ups, SPI Flash, Accelerometer, etc,).  However it should be noted that in this configuration, P3V3_BRD will be back-powered through resistor R90.  R90 is a 180kOhm resistor that connects directly to the MCU reset pin.  This R90 also connects to V_TGTMCU which is directly connected to P3V3_BRD through shorting trace SH500.  The internal pull-up on the reset pin will, in this case, power P3V3_BRD.      Impact:  Customers will not be able to isolate the MCU IDD current from the board peripherals when measuring current in the buck mode configuration.  This is a problem mostly when attempting to achieve datasheet IDD current numbers for low power modes in buck mode.   Workaround:  There are currently three (3) workarounds for this issue. Remove resistor R90. Cut shorting trace SH500. Customers should exercise caution when using this workaround.  After cutting this short trace, the OpenSDA interface buffers would no longer be powered.  Therefore, OpenSDA programming and serial communication will not be possible even when J8 shorting jumper is placed.   Disable the reset pin in the FOPT field then configure the pin, PTA2, for GPIO output functionality driven low.  Customers should exercise caution when implementing this option.  The pin, PTA2, could be used as a GPIO in the end application in this configuration, but you would not want to drive PTA2 high while SW1 was directly connected to PTA2 through pins 2 and 3 of jumper J24.  In this situation, you potentially short VDD and VSS inadvertently by pressing SW1.  If using this workaround, it is recommended to ensure the shorting jumper of J24 is either removed or connected to pins 1 and 2.    4) Incorrect routing of SWD clock for stand-alone debugger configuration Issue:  The signal SWD_CLK_TGTMCU  is incorrectly routed to pin 1 of connector J12 instead of pin 4 of the SWD connector, J9.     Impact:  With this routing, when the OpenSDA circuit is configured as a stand-alone debugger for debugging other targets (i.e., when J12's shorting trace is cut), the OpenSDA SWD clock will not be able to be present on pin 4 of connector J9. Therefore, the FRDM-KW41Z cannot act as a stand-alone debugger to facilitate debugging other systems.   Workaround:  There is currently only one workaround for this issue.  The workaround is a hardware workaround that requires a cutting tool (such as a modeler's knife), soldering iron, solder, and a spare wire.  To implement the workaround, follow these instructions.   Cut trace J12.                                                                                                                                                                            Cut the trace next to pin 2 and 4 of J9 that connects J9, pin 4 to J12, pin 2. Once this is done, be sure to use a multimeter and ensure there is no electrical connection between J12, pin 2, and J9, pin 4.                                                                                                          Solder one end of a spare wire to J9, pin 4, and the other end of the spare wire to J12, pin 1.  This should be done on the bottom of the board.  
記事全体を表示
This document provides the calculation of the Bluetooth Low Power consumption linked to the setting of the Kinetis.   The Power Profile Calculator is build to provide the power consumption of your application. It's a mix between real measurements in voltage and temperature. The process is not taken into account which may create some variation.   DISCLAIMER: This excel workbook is provided as an estimation tool for NXP customers and is based on power profile measurements done on a set of randomly selected parts. A specific part may exhibit deviation from the nominal measurements used on this tool.   This document is the summary of all the information available in the AN12459 Power Consumption Analysis - FRDM-KW38 available in the NXP web page.   Several parameters could be fill-in: Buck or bypass mode (DCDC) Supply Voltage (2.4V to 3.6V) Temperature (-40°C to +105°C) Processor configuration (20MHz, 32MHz or 48MHz) 10 different deep sleep modes Different Tx output power (0dBm, +3.5dBm or +5dBm) Data rate (1Mbps, 2Mbps, 500kbps, 125kbps) Possibility to set the Advertising interval, connection interval, scan interval and active scan windows duration Fix the Bluetooth Packet sizes in Advertising and Connection  Tx/Rx payload.   One optional information is to provide an idea of the duration life time on 9 typical batteries.
記事全体を表示
This application note describes the usage of the DC-DC Switching Mode Power Supply (SMPS) converter for the MKW39A/38A/37A/38Z/37Z families. This document covers operating voltages, types of circuit operation, hardware design guidelines, software configuration, and power capabilities. It's a complementary document from the AN5025. The DC-DC converter for MKW3x is a dual output converter that supports two operating modes: Bypass and Buck. In Bypass mode, the DC-DC converter is disabled and the supply pins of the microcontroller must be supplied externally. In Buck mode, the DC-DC converter is enabled and requires a DC supply in the range of 1.8 V to 4.2 V (during startup the minimum required is 2.1 V).
記事全体を表示
As mentioned in this other post, its important to have the correct trim on the external XTAL. However, once you have found the required trim to properly adjust the frequency, it is not very practical to manually adjust it in every device. So here is where changing the default XTAL trim comes in handy. KW41Z With the KW41 Connecitivity Software 1.0.2, it is a pretty straightforward process. In the hardware_init.c file, there is a global variable mXtalTrimDefault. To change the default XTAL trim, simply change the value of this variable. Remember it is an 8 bit register, so the maximum value would be 0xFF. KW40Z With the KW40, it is a similar process; however, it is not implemented by default on the KW40 Connectivity Software 1.0.1, so it should be implemented manually, following these steps: Create a global variable in hardware_init.c to store the default XTAL trim, similar to the KW41:  /* Default XTAL trim value */ static const uint8_t mXtalTrimDefault = 0xBE;‍‍‍‍‍‍‍‍ Overwrite the default XTAL trim in the hardware_init() function, adding these lines after NV_ReadHWParameters(&gHardwareParameters):    if(0xFFFFFFFF == gHardwareParameters.xtalTrim)   {       gHardwareParameters.xtalTrim = mXtalTrimDefault;   }‍‍‍‍‍‍‍‍‍‍‍‍ Add this define to allow XTAL trimming in the app_preinclude.h file:  /* Allows XTAL trimming */ #define gXcvrXtalTrimEnabled_d  1‍‍‍‍‍‍‍ Once you have found the appropriate XTAL trim value, simply change it in the global variable declared in step 1.
記事全体を表示
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343043
記事全体を表示
Hello community, This time I bring to you a document which explains how easy is to add a new endpoint and a new cluster to a ZigBee device in the BeeStack in BeeKit. This document is based in the MC1323x MCUs but the procedure applies to the Kinetis devices. Before to start you need to install the BeeKit Wireless Connectivity Toolkit​. If you are interested about what an endpoint is, the document ZigBee Endpoints Reserved could be useful for you. I hope you find this guide useful. Enjoy this guide, enjoy ZigBee! Any feedback is welcome. Best regards, Earl Orlando Ramírez-Sánchez Technical Support Engineer NXP Semiconductors
記事全体を表示
Introduction When a software update is requested by an OTAP Client (a device that receives a software update, commonly Bluetooth LE Peripheral) from the OTAP Server (a device that sends a software update, commonly Bluetooth LE Central), you may want to preserve some data previously acquired, such as bonding information, trimming values for the system oscillators, or probably NVM data for your application. This document guides you in performing OTAP updates preserving the flash data content of your interest. This document is intended for developers familiarized with OTAP custom Bluetooth LE service, for more information, you can take a look at the following post: Reprogramming a KW36 device using the OTAP Client Software.   OTAP Header and Sub-elements OTAP Protocol implements a format for the software update that is composed of a header and a defined number of sub-elements. The OTAP Header describes general information about the software update and it has a defined format shown in the following figure. For more information about the header fields, you can go to 11.4.1 Bluetooth Low Energy OTAP header chapter of the Bluetooth Low Energy Application Developer's Guide document included in the SDK at <SDK_2.2.X_FRDM-KW36_Download_Path>\docs\wireless\Bluetooth                              Each Sub-element contains information for a specific purpose. You could implement your proprietary fields for your application (For more information about sub-element fields, you can go to 11.4.1 Bluetooth Low Energy OTAP header chapter of the Bluetooth Low Energy Application Developer's Guide document included in the SDK at <SDK_2.2.X_FRDM-KW36_Download_Path>\docs\wireless\Bluetooth). OTAP includes the following sub-elements: Image File Sub-element Value Field Lenght (bytes) Description Upgrade Image  Variable This sub-element contains the actual binary executable image which is copied into the flash memory of the OTAP Client device. The maximum size of this sub-element depends on the target hardware. Sector Bitmap 32 This sub-element contains a sector bitmap of the flash memory of the target device which tells the bootloader which sectors should be overwritten and which leave intact. The format of this field is the least-significant bit first for each byte with the least significant bytes and bits standing for the lowest memory sections of the flash.  Image File CRC 2 This is a 16-bit CRC calculated over all elements of the image file except this field itself. This element must be the last sub-element in an image file sent over the air.   OTAP Sector Bitmap Sub-element Field The KW36 Flash is partitioned into: One 256 KB Program Flash (P-Flash) array divided into 2 KB sectors with a flash address range from 0x0000_0000 to 0x0003_FFFF. One 256 KB FlexNVM array divided in 2 KB sectors, flash address ranges from 0x1000_0000 to 0x1003_FFFF with an Alias memory with address range 0x0004_0000 to 0x0007_FFFF. The Bitmap sub-element is 256 bits of length, in terms of the KW36 flash, each bit represents a 2KB sector covering the address range from 0x0 - 0x0007_FFFF (P-Flash to FlexNVM Alias address range), where 1 means that such sector should be erased and 0 means that such sector should be preserved. The Bitmap field is used by the OTAP Bootloader to obtain the address range which should be erased before programming the KW36 with the software update, so it must be configured before sending a software update to leave intact the address range of memory that contain data of your interest and erase only the address range that will be overwritten by the software update.        For example: Suppose that a developer wants to preserve the address range between 0x7D800 - 0x7FFFF and the address range between 0x0 - 0x1FFF, and the left memory must be erased. The address range between 0x7D800 - 0x7FFFF corresponds to the 5 top flash sectors and the address range between 0x0 - 0x1FFF is the lowest 4 sectors. So, it means that bits between 256 and 252 (256, 255, 254, 253 and 252) and bits between 4 and 1 (4,3,2 and 1) should be set to 0, that way OTAP Bitmap for this example is: 0x07FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF0   Configuring OTAP Bitmap to Protect an Address Range with NXP Test Tool Download and install Test Tool for Connectivity products in NXP's web site Open NXP Test Tool 12 software on your PC. Go to "OTA Updates -> OTAP Bluetooth LE" Then load your image file for the software update clicking on the "Browse..." button (NXP Test Tool only accepts .bin and .srec files). You can configure the OTAP Bitmap selecting the "Override sector bitmap" checkbox and changing the default value by your new bitmap value. Once you have configured the bitmap, select "Save...".   Then, a window will be displayed to select the destination to save the .bleota file. Provide a name to identify this file. You can use this file with IoT Toolbox App for Android and iOS to update the software using OTAP. This new .bleota file contains the bitmap that tells to the OTAP Bootloader which sectors will be erased and which sectors will be preserved.          
記事全体を表示
The KW40Z has support for a 32 MHz reference oscillator. This oscillator is used, among other things, as the clock for the RF operation. To properly adjust the frequency provided by this oscillator, there is a register that can be written, and this register (XTAL_TRIM) adjusts the capacitance provided by the internal capacitor bank to which the oscillator is connected. The KW40Z comes preprogramed with a default value (0x77) in the XTAL_TRIM register. However, since there is probably some variance when using different HW, the central frequency should be verified using a spectrum analyzer. Depending on the value measured, the XTAL_TRIM register can be modified to adjust the frequency. The Connectivity Test application provided here was modified, adding support to change the XTAL_TRIM register. In this case, the Agilent Technologies N9020A MXA Signal Analyzer was used, configured with the following parameters: FREQ (central frequency): 2405 MHz (test will be conducted on channel 11) SPAN (x-axis): 100 KHz AMPTD (amplitude, y-axis): 5 dBm   To perform the test, program the KW40Z device with the Connectivity Test application, using the provided .bin file, or using IAR and replacing the files in the project with the ones provided. To replace the files, unzip the provided .zip file in the KW40Z Connectivity Software folder and when asked, select to replace the existing files with the new ones. To measure and adjust the trimming, run the Connectivity Test application. Press ENTER to start the application. Press 1 to select the continuous tests mode. Press 4 to start a continuous unmodulated transmission. Once the test is running, you should be able to see the unmodulated signal in the spectrum analyzer. Use D and F to change the XTAL_TRIM value, thus changing the central frequency. Now, considering the test is being performed in channel 11, the central frequency should be centered exactly in 2.405 GHz, but on this board, for example, it is slightly above (2.4050259 GHz) by default. In order to fix this, you will need to adjust the value of the XTAL_TRIM register. As you change the XTAL_TRIM value, the central frequency changes too. Adjust the trim value until you find a value that moves the frequency to where it should be centered. For this particular board, a trimming value of 189 (0xBD) was used. Once you have found the trimming value that best adjusts the frequency, you can use it in other projects using the following function, included in the KW4xXcvrDrv.h file: XcvrSetXtalTrim(<YOUR 8 BIT XTAL_TRIM VALUE>)‍‍‍‍‍‍
記事全体を表示
This article will describe in detailed steps how to generate, build and test a Bluetooth low energy Heart Rate Sensor project on the FRDM-KW41Z evaluation board by using the Bluetooth Developer Studio (BDS) and the NXP Kinetis BDS Plug-in. Getting Started To use this plug-in and test its output, the following programs are required:  - Bluetooth Developer Studio v1.1.306 or newer: Bluetooth Developer Studio & Plugins | Bluetooth Technology Website   - NXP Semiconductors Kinetis Plug-in v1.0.0: Link  - Kinetis SDK 2.0 with support for MKW41Z and Bluetooth Stack version 1.2.2: Link  - Kinetis SDK 2.0 add-on for BDS (found in the same package as the plug-in)  - Kinetis BLE Toolbox Android or iOS mobile application To enable the NXP Kinetis BDS Plug-in in the Bluetooth Developer Studio, follow please the installation details in the readme.txt document included in the downloaded plug-in archive. Creating the project with BDS Create a new project by clicking FILE-> NEW PROJECT. Add project location, name and namespace as detailed below: Drag and drop an adopted Heart Rate Profile from the right hand side list. Your device should import the following services:   Next step will be to configure the GAP layer. Click on the GAP button. First tab will be the Advertising Data. Enter desired values and check which AD types you want to include in the advertising packets. A bar below will show you how much bytes your data uses. Make sure you do not use more than the 32 bytes available. Next step is to configure the GAP properties. Make sure you check at least one advertising channel and a reasonable advertising interval range, as presented below:     Click TOOLS->GENERATE CODE. Select Server as GATT side to be generated and NXP Semiconductors Kinetis v1.0.0 as the plug-in. BDS will prompt you to enter a location for the exported files. After generating the files, another window with the results log will appear. If no error messages appear, the generation is successful. Check the “Open output location when finished” box and hit the “Finish” button. A folder with the following content will open: Using the generated code Copy the contents inside the following folder:  "<SDK 2.0 installation folder>\middleware\wireless\bluetooth_1.2.2\examples\bds_template_app". To generate the “bds_template_app” embedded project and test it, follow the instructions detailed in the Bluetooth Quick Start Guide document from the SDK. Seeing the application in action Before compiling the application add the following code snippet in app.c inside BleApp_HandleKeys:         case gKBD_EventPressPB2_c:         {             mUserData.cRrIntervals = 0;             mUserData.expendedEnergy = 100;             Hrs_RecordHeartRateMeasurement(service_heart_rate, 120, &mUserData);             break;         } This will allow the board to send heart rate data of 120 bpm while in a connection and when pressing button SW3 on the FRDM-KW41Z board. The value can be seen when using Kinetis BLE Toolbox, as shown below:
記事全体を表示
Introduction The FRDM-KW36 includes an RTC module with a 32 kHz crystal oscillator. This module generates a 32 kHz clock source for the MCU whilst running on very low power mode. This oscillator includes a set of programmable capacitors used as the C LOAD . Changing the value of these capacitors can modify the frequency the oscillator provides. This configurable capacitance ranges from 0 pF (capacitor bank disabled) to 30 pF in steps of 2 pF. These values are obtained by combining the enabled capacitors. The values available are 2 pF, 4 pF, 8 pF, and 16 pF. Any combination of these four can be done. It is recommended that these internal capacitors are disabled if the external capacitors are available (clearing SC2P, SC4P, SCS8, and SC16 bits in RTC Control Register SFR). To adjust the frequency provided by the oscillator, you must first be able to measure the frequency. Using a frequency counter would be ideal, as it provides a more precise measurement than an oscilloscope. You will also need to output the oscillator frequency. To output the oscillator frequency, using any of the Bluetooth demo applications as an example, you should do the following: Adjusting Frequency Example This example will make use of the Heart Rate Sensor demo (freertos version) from the Connectivity Software Stack and assumes that the developer has the knowledge of import or open projects from the SDK to IDE. Open or clone the Heart Rate Sensor project from your SDK. Find the board.c and board.h files in the board folder at the workspace.                                                                                Declare a void function on the board.h file as shown below. This function will be in order to mux the RTC clock out to the PTB3 and be able to measure the frequency.  /* Function to mux PTB3 to RTC_CLKOUT */ void BOARD_EnableRtcClkOut (void);‍‍ Develop the BOARD_EnableRtcClkOut function inside the board.c file as below. void BOARD_EnableRtcClkOut(void) { /* Enable PORTB clock gating */ CLOCK_EnableClock(kCLOCK_PortB); /* Mux the RTC_CLKOUT to PTB3 */ PORT_SetPinMux(PORTB, 3u, kPORT_MuxAlt7); /* Select the 32kHz reference for RTC_CLKOUT signal */ SIM->SOPT1 |= SIM_SOPT1_OSC32KOUT(1); } Call the BOARD_EnableRtcClkOut function in hardware_init function just after BOARD_BootClockRUN (board.c file). Find clock_config.c file in the board folder at the workspace. Add the following defines at the top of the file. #define RTC_OSC_CAP_LOAD_0 0x0U /*!< RTC oscillator, capacitance 0pF */ #define RTC_OSC_CAP_LOAD_2 0x2000U /*!< RTC oscillator, capacitance 2pF */ #define RTC_OSC_CAP_LOAD_4 0x1000U /*!< RTC oscillator, capacitance 4pF */ #define RTC_OSC_CAP_LOAD_6 0x3000U /*!< RTC oscillator, capacitance 6pF */ #define RTC_OSC_CAP_LOAD_8 0x800U /*!< RTC oscillator, capacitance 8pF */ #define RTC_OSC_CAP_LOAD_10 0x2800U /*!< RTC oscillator, capacitance 10pF */ #define RTC_OSC_CAP_LOAD_12 0x1800U /*!< RTC oscillator, capacitance 12pF */ #define RTC_OSC_CAP_LOAD_14 0x3800U /*!< RTC oscillator, capacitance 14pF */ #define RTC_OSC_CAP_LOAD_16 0x400U /*!< RTC oscillator, capacitance 16pF */ #define RTC_OSC_CAP_LOAD_18 0x2400U /*!< RTC oscillator, capacitance 18pF */ #define RTC_OSC_CAP_LOAD_20 0x1400U /*!< RTC oscillator, capacitance 20pF */ #define RTC_OSC_CAP_LOAD_22 0x3400U /*!< RTC oscillator, capacitance 22pF */ #define RTC_OSC_CAP_LOAD_24 0xC00U /*!< RTC oscillator, capacitance 24pF */ #define RTC_OSC_CAP_LOAD_26 0x2C00U /*!< RTC oscillator, capacitance 26pF */ #define RTC_OSC_CAP_LOAD_28 0x1C00U /*!< RTC oscillator, capacitance 28pF */ #define RTC_OSC_CAP_LOAD_30 0x3C00U /*!< RTC oscillator, capacitance 30pF */ Search the CLOCK_CONFIG_EnableRtcOsc call to a function inside the BOARD_BootClockRUN function (also in the clock_config.c file), and edit the argument by any of the defines above. Finally, disable the low power options and led support in the "preinclude.h" file located in the source folder of the project: #define cPWR_UsePowerDownMode 0 #define gLEDSupported_d 0 At this point, you can measure in PTB3 and play with the frequency adjust using your frequency counter. Each time that the board is programmed, you need to perform a POR to get the correct measure. The following table was obtained from an FRDM-KW36 board rev B and it can be used as a reference to adjust the frequency. Please note that the capacitance is not only composed of the enabled internal capacitance, but also the parasitic capacitances found in the package, bond wires, bond pad, and the PCB traces. So, while the reference measurements given below should be close to the actual value, you should also make measurements with your board, to ensure that the frequency is trimmed specifically to your board and layout.   Enabled Capacitors CLOAD Capacitance Definition Frequency - 0pF RTC_OSC_CAP_LOAD_0 (bank disabled) 32772.980Hz SC2P 2pF RTC_OSC_CAP_LOAD_2 32771.330Hz SC4P 4pF RTC_OSC_CAP_LOAD_4 32770.050Hz SC2P, SC4P 6pF RTC_OSC_CAP_LOAD_6 32769.122Hz SC8P 8pF RTC_OSC_CAP_LOAD_8 32768.289Hz SC2P, SC8P 10pF RTC_OSC_CAP_LOAD_10 32767.701Hz SC4P, SC8P 12pF RTC_OSC_CAP_LOAD_12 32767.182Hz SC2P, SC4P, SC8P 14pF RTC_OSC_CAP_LOAD_14 32766.766Hz SC16P 16pF RTC_OSC_CAP_LOAD_16 32766.338Hz SC2P, SC16P 18pF RTC_OSC_CAP_LOAD_18 32766.038Hz SC4P, SC16P 20pF RTC_OSC_CAP_LOAD_20 32765.762Hz SC2P, SC4P, SC16P 22pF RTC_OSC_CAP_LOAD_22 32765.532Hz SC8P, SC16P 24pF RTC_OSC_CAP_LOAD_24 32765.297Hz SC2P, SC8P, SC16P 26pF RTC_OSC_CAP_LOAD_26 32765.117Hz SC4P, SC8P, SC16P 28pF RTC_OSC_CAP_LOAD_28 32764.940Hz SC2P, SC4P, SC8P, SC16P 30pF RTC_OSC_CAP_LOAD_30 32764.764Hz
記事全体を表示
Thread provides basic services required for application frameworks implementation with the usage of Unicast and Multicast transmissions over UDP. Thread specification is only focused on the network layer; many application layers can be designed to run without any problem as it is application layer agnostic.  In this laboratory the user will work with the Constrain Application Protocol (CoAP) for this application layer as the Thread stack uses CoAP for most of the multi-hop network management and commissioning messages. The Constrained Application Protocol (CoAP) is a specialized web transfer protocol to use with constrained nodes and constrained networks in the Internet of Thing.  It uses a binary RESTful protocol with four methods POST GET PUT DELETE CoAP also uses ACK responses; CONfirmable (ACK requested) and NONconfirmable messages. The Thread stack uses CoAP for the majority of multi-hop network management and commissioning messages   Objectives Through this laboratory the user will modify the firmware to achieve the following list: Add 2 new COAP URI resources “/resource1” and “/resource2”. Send an ACK message in “/resource1” in case a CON request was received as specified by the CoAP standard. Include a default payload in the ACK message. All packets destined to “/resource1” will trigger a NON POST packet reply (independent from the expected ACK packet) destined to “/resource2” URI path with a default payload. Print in shell all CoAP transactions to fully understand when a request was sent and when a response was received, indicating the method and the resource, e.g. If a CON POST was received, print on shell “‘NON’ packet received, ‘POST’ with payload of ‘<payload>’ If a NON POST was sent, print on shell “‘NON’ packet sent, ‘POST’ with payload ‘<payload>’ The process desired behavior by the laboratory is shown in figure 1.   Figure 1 Diagram showing the desired behavior of the laboratory   Setup In the following list, the components with a dash (—) will be the ones used to create this laboratory.   2 FRDM-KW41Z       — Rev.  A Connectivity Software from the latest NXP release.       — Thread Router Eligible Device project Serial Terminal       — TeraTerm   Figure 2 FRDM-KW41Z    Modifying Firmware       The following changes will be made in the router_eligible_device_app.c file.  1. Define the URI path names that will be used in the shell to access the resources. #define APP_RESOURCE1_URI_PATH                       "/resource1" #define APP_RESOURCE2_URI_PATH                       "/resource2" 2. Declare the URI resources with coapUriPath_t. When using this struct the user must enter the length of the URI path and the path created in the last step. const coapUriPath_t gAPP_RESOURCE1_URI_PATH = {SizeOfString(APP_RESOURCE1_URI_PATH), APP_RESOURCE1_URI_PATH}; const coapUriPath_t gAPP_RESOURCE2_URI_PATH = {SizeOfString(APP_RESOURCE2_URI_PATH), APP_RESOURCE2_URI_PATH}; 3. Create the callbacks for the resources. This callbacks will handle the packet received and perform the desired action depending on the type of COAP method received. static void APP_CoapResource1Cb(coapSessionStatus_t sessionStatus, void *pData, coapSession_t *pSession, uint32_t dataLen); static void APP_CoapResource2Cb(coapSessionStatus_t sessionStatus, void *pData, coapSession_t *pSession, uint32_t dataLen); 4. Add the callback handler for the packet received, in this function it will be defined which action will be performed depending on the type of COAP method received. APP_CoapResource1Cb static void APP_CoapResource1Cb ( coapSessionStatus_t sessionStatus, void *pData, coapSession_t *pSession, uint32_t dataLen ) {   static uint8_t pMySessionPayload[3]={0x31,0x32,0x33};   static uint32_t pMyPayloadSize=3;   coapSession_t *pMySession = NULL;   pMySession = COAP_OpenSession(mAppCoapInstId);   COAP_AddOptionToList(pMySession,COAP_URI_PATH_OPTION, APP_RESOURCE2_URI_PATH,SizeOfString(APP_RESOURCE2_URI_PATH));     if (gCoapConfirmable_c == pSession->msgType)   {     if (gCoapGET_c == pSession->code)     {       shell_write("'CON' packet received 'GET' with payload: ");     }     if (gCoapPOST_c == pSession->code)     {       shell_write("'CON' packet received 'POST' with payload: ");     }     if (gCoapPUT_c == pSession->code)     {       shell_write("'CON' packet received 'PUT' with payload: ");     }         if (gCoapFailure_c!=sessionStatus)     {       COAP_Send(pSession, gCoapMsgTypeAckSuccessChanged_c, pMySessionPayload, pMyPayloadSize);     }   }   else if(gCoapNonConfirmable_c == pSession->msgType)   {     if (gCoapGET_c == pSession->code)     {       shell_write("'NON' packet received 'GET' with payload: ");     }     if (gCoapPOST_c == pSession->code)     {       shell_write("'NON' packet received 'POST' with payload: ");     }     if (gCoapPUT_c == pSession->code)     {       shell_write("'NON' packet received 'PUT' with payload: ");     }      }   shell_writeN(pData, dataLen);   shell_write("\r\n");   pMySession -> msgType=gCoapNonConfirmable_c;   pMySession -> code= gCoapPOST_c;   pMySession -> pCallback =NULL;   FLib_MemCpy(&pMySession->remoteAddr,&gCoapDestAddress,sizeof(ipAddr_t));   COAP_SendMsg(pMySession,  pMySessionPayload, pMyPayloadSize);   shell_write("'NON' packet sent 'POST' with payload: ");   shell_writeN((char*) pMySessionPayload, pMyPayloadSize);   shell_write("\r\n"); } There can be one COAP instance per UDP port, in case the application only uses one port, one instance will be enough. There can be multiple COAP sessions per instance, a COAP session is per packet/transaction. In this case as the desired result was to have a different response of the ACK, it will be necessary to create a new session with the new resource. APP_CoapResource2Cb   static void APP_CoapResource2Cb ( coapSessionStatus_t sessionStatus, void *pData, coapSession_t *pSession, uint32_t dataLen ) {   if (gCoapNonConfirmable_c == pSession->msgType)   {       shell_write("'NON' packet received 'POST' with payload: ");        shell_writeN(pData, dataLen);       shell_write("\r\n");   }  } 5. After creating the callbacks, those must be registered in the CoAP callback array in the function APP_InitCoapDemo(void) {APP_CoapResource1Cb, (coapUriPath_t*)&gAPP_RESOURCE1_URI_PATH}, {APP_CoapResource2Cb, (coapUriPath_t*)&gAPP_RESOURCE2_URI_PATH},   There are some things to mention of the usage of the CoAP library that were not used for this laboratory but might be useful for other types of applications. When using COAP_SendMsg() the session will close automatically by default unless it is indicated with the usage of pSession->autoClose. There are two options while sending the message: Confirmable (CON): It waits for an ACK reply and until it gets the message it will close the session or it will close the session when retransmissions are exhausted. Non-confirmable (NON): For NON, immediately after sending the message. In case a message was sent and there was no response a retransmission will be sent each COAP_ACK_TIMEOUT (in miliseconds), the retransmissions are sent exponentially: first after random (2, 3) seconds, next doubles the timeout and so on, until COAP_MAX_RETRANSMIT is reached. After retransmissions stop, the session is automatically closed and informs the application of failure the application callback will be called with status gCoapFailure_c. When the callback is called the current session is still valid, but CoAP session will close it after exiting the function. There are two different work this out: A new session must be created Set pSession->autoClose = FALSE. If autoClose is set to FALSE, without forgetting to close the session from application, using COAP_CloseSession().     Running the demo    1. Download the modified firmware in the boards 2. Open a serial terminal for each board with a baud rate of 115200 Figure 3 Serial terminal and its configuration  3. In one of the board’s terminal type “thr create”, this board will be the leader. Figure 4 Board 1 with command "thr create" Figure 5 Board 1 after the command "thr create"   4. Once the network has been created type “thr join” in the second board’s terminal. Figure 6 Board 2 with command "thr join" Figure 7 Board 2 after command "thr join" 5. In both serial terminals type the command “ifconfig”. This command will display all the addresses of the board. Figure 8 Board 1 after command "ifconfig" Figure 9 Board 2 after command "ifconfig"   6. To test the callbacks created, a CoAP message must be sent. The following command must be typed; coap <type> <method> <address> <URI> <payload>                                                                                      coap CON POST fe80::5df0:2bf0:d69b:1b3c  /resource1 hello                                                                                      Figure 10 CoAP command to send 7. The result of sending must look like : — Board 1 The board 1 will request the board 2 the resource1 Figure 11 Board 1 before sending the CoAP command As it was coded the other board will send an ACK and print the message. Figure 12 Board 1 after sending the CoAP command — Board 2 Figure 13 Board 2 after receiving the CoAP command If using the CON message the requester board will receive a response, while if the message is a NON type it will not have the response.   When using this types of messages independently of the package type when sending a message a new session will be open and it will send a NON type of message.
記事全体を表示
Introduction This document is to guide how to modify the OTAP Client software to the Low Power module. The starting point of this document is the OTAP Client example in the FRDM-KW36 SDK v2.2.2.   Deep Sleep Modes This section provides a base to understand how the developer should change between DSM1 (Deep Sleep Mode 1) and DSM3 (Deep Sleep Mode 3). The DSM6 does not need to be started by the developer, instead, the controller configures this mode automatically and returns to the latest mode after finished the radio activity.   DSM1 This low-power mode was designed to be used when the BLE stack is active, in other words when the LL is in advertising, scanning, or connection states. In this mode, the MCU enters LLS3 and BLE Link Layer enters deep sleep. The SoC wakes up from this mode by the on-board switches, by LPTMR timeout, or by BLE Link Layer wake-up interrupt (BLE_LL reference clock reaches wake up instance register) using LLWU module. The LPTMR timer is used to measure the time that the MCU spends in deep sleep to synchronize low-power timers at wakeup.   DSM3 This low-power mode was designed to be used when all stacks enabled for this platform are idle, in other words, when the LL stop advertising, scanning, or connection. In this mode, the MCU enters LLS3 and all enabled link layers remain idle. All RAM is retained. The SoC wakes up from this mode by the on-board switches, by DCDC power switch (when DCDC is in buck mode), or by LPTMR timeout using LLWU module. The LPTMR timer is also used to measure the time that MCU spends in deep sleep to synchronize low-power timers at wakeup.   DSM6 This low-power mode was developed to save some power while the radio is on. Its most common use case is with the radio in Rx waiting for a packet. Upon receiving the packet the radio wakes up the MCU. In this mode, the MCU enters STOP mode and the radio maintains its state. Any module capable of producing an interrupt can wake up the MCU, such as on-board switches, DCDC power switch (when DCDC is in buck mode), LPTMR timeout, Radio Interrupt, UART, and so on. The LPTMR timer is also used to measure the time that the MCU spends in deep sleep to synchronize low-power timers at wakeup.   For more information about DSM modes, you can inspect the “Connectivity Framework Reference Manual” chapter 3.15 Low-power library, it provides full information of Low Power modes and the usage on the NXP stack. It is available in your SDK at <FRDM-KW36 SDK root>\docs\wireless\Common.   Modifications on the Software In order to add low power on the OTAP Client (switching between DSM1, DSM3, and DSM6) two files must be modified: - app_preinclude.h - otap_client_att.c The following sections explain these changes.   app_preinclude.h This file is intended to contain the definitions that manage the behavior of the application. To include and enable the Low Power module you must add (or modify if the macro is already defined in this file) the following preprocessor directives.   1. Modify the AppPoolsDetails as following. /* Defines pools by block size and number of blocks. Must be aligned to 4 bytes.*/ #define AppPoolsDetails_c \ _block_size_ 32 _number_of_blocks_ 6 _eol_ \ _block_size_ 64 _number_of_blocks_ 4 _eol_ \ _block_size_ 88 _number_of_blocks_ 3 _eol_ \ _block_size_ 248 _number_of_blocks_ 2 _eol_ \ _block_size_ 312 _number_of_blocks_ 1 _eol_ \ _block_size_ 392 _number_of_blocks_ 1 _eol_‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ 2. Set “cPWR_UsePowerDownMode” to 1 and keep the following directives in the “Framework Configuration” section as shown below. /* Check Low Power Timer */ #define cPWR_CheckLowPowerTimers 1 /* Enable/Disable Low Power Timer */ #define gTMR_EnableLowPowerTimers 1 /* Enable/Disable PowerDown functionality in PwrLib */ #define cPWR_UsePowerDownMode 1 /* Enable/Disable BLE Link Layer DSM */ #define cPWR_BLE_LL_Enable 1 /* Default Deep Sleep Mode*/ #define cPWR_DeepSleepMode 3 /* Enable/Disable MCU Sleep During BLE Events */ #define cMCU_SleepDuringBleEvents 1 /* Default deep sleep duration in ms */ #define cPWR_DeepSleepDurationMs 30000 /* Number of slots(625us) before the wake up instant before which the hardware needs to exit from deep sleep mode. */ #define cPWR_BLE_LL_OffsetToWakeupInstant 3 /* Enables / Disables the DCDC platform component */ #define gDCDC_Enabled_d 1 /* Default DCDC Mode used by the application */ #define APP_DCDC_MODE gDCDC_Mode_Buck_c /* Default DCDC Battery Level Monitor interval */ #define APP_DCDC_VBAT_MONITOR_INTERVAL 600000‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ 3. Add the following directives in the “BLE Stack Configuration” section. Create the “Auto Configuration” section to disable LED support whenever Low Power is enabled. /*! ********************************************************************************* * BLE Stack Configuration ********************************************************************************** */ /* Time between the beginning of two consecutive advertising PDU's */ #define mcAdvertisingPacketInterval_c 0x02 /* 1.25 msec */ /* Offset to the first instant register. */ #define mcOffsetToFirstInstant_c 0x00 /* 625usec */ /*! ********************************************************************************* * Auto Configuration ********************************************************************************** */ /* Disable LEDs when enabling low power */ #if cPWR_UsePowerDownMode || gMWS_UseCoexistence_d #define gLEDSupported_d 0 #endif #if gMWS_UseCoexistence_d #undef gKBD_KeysCount_c #define gKBD_KeysCount_c 1 #endif‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ 4. Modify the “Memory Pools Configuration” section as follows. /* Enable RNG seed storage in Flash */ #define gRngSeedStorageAddr_d ((uint32_t)FREESCALE_PROD_DATA_BASE_ADDR + 1024) /* Enable XCVR calibration storage in Flash */ #define gPreserveXcvrDacTrimValue_d 1 #define gXcvrDacTrimValueSorageAddr_d ((uint32_t)FREESCALE_PROD_DATA_BASE_ADDR + 1040) /* Application Connection sleep mode */ #define gAppDeepSleepMode_c 1 /* Application RAM usage configuration */ #define cPWR_RamRetentionInVLLS 2 /* 32K */ /* Disable unused LowPower modes */ #define cPWR_EnableDeepSleepMode_1 1 #define cPWR_EnableDeepSleepMode_2 0 #define cPWR_EnableDeepSleepMode_3 1 #define cPWR_EnableDeepSleepMode_4 0 #define cPWR_EnableDeepSleepMode_5 0 #define cPWR_EnableDeepSleepMode_7 0 #define cPWR_EnableDeepSleepMode_8 0 /* Warm-boot sequence will use the default stack which is used by ISRs on FreeRTOS */ #define USE_WARMBOOT_SP 0‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   otap_client_att.c This is the main source file at the application level. Here are managed all the procedures that the device performs, before, during, and after to create a connection. This allows you to get the state of the device any instant and, hence, the dedicated low power APIs that rule the application must be implemented here, in the callbacks contained in this file, for an easier switching among the low power states.   1. Include “PWR_Configuration.h” header in “Include” section: #if (cPWR_UsePowerDownMode) #include "PWR_Interface.h" #include "PWR_Configuration.h" #endif‍‍‍‍‍‍‍‍‍‍‍‍ 2. Locate the “BleApp_Config” function. This function is executed once, after POR (Power on reset) during the device setup. Here you can change the deep sleep mode to DSM3 and allow the device to sleep using “PWR_ChangeDeepSleepMode” and “PWR_AllowDeviceToSleep” APIs. When the device has finished the initialization, it goes to sleep since all stacks are idle. See the following example. static void BleApp_Config(void) { #if defined(MULTICORE_APPLICATION_CORE) && (MULTICORE_APPLICATION_CORE == 1) if (GattDbDynamic_CreateDatabase() != gBleSuccess_c) { panic(0,0,0,0); return; } #endif /* MULTICORE_APPLICATION_CORE */ /* Common GAP configuration */ BleConnManager_GapCommonConfig(); /* Register stack callbacks */ (void)App_RegisterGattServerCallback (BleApp_GattServerCallback);‍‍‍‍‍‍‍‍‍‍‍‍‍ mAdvState.advOn = FALSE; /* Start services */ basServiceConfig.batteryLevel = BOARD_GetBatteryLevel(); (void)Bas_Start(&basServiceConfig); (void)Dis_Start(&disServiceConfig); if (OtapClient_Config() == FALSE) { /* An error occurred in configuring the OTAP Client */ panic(0,0,0,0); } /* Allocate application timer */ appTimerId = TMR_AllocateTimer(); mBatteryMeasurementTimerId = TMR_AllocateTimer(); #if (cPWR_UsePowerDownMode) #if MULTICORE_APPLICATION_CORE #if gErpcLowPowerApiServiceIncluded_c PWR_ChangeBlackBoxDeepSleepMode(cPWR_DeepSleepMode); PWR_AllowBlackBoxToSleep(); #endif PWR_ChangeDeepSleepMode(cPWR_DeepSleepMode); PWR_AllowDeviceToSleep(); #else PWR_ChangeDeepSleepMode(cPWR_DeepSleepMode); PWR_AllowDeviceToSleep(); #endif #endif }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ 3. Locate the “BleApp_Start” function. This function is executed just after wake up by pressing the LLWU SW3 button. This action will trigger the advertising, so, you must change the deep sleep mode to DSM1 using “PWR_ChangeDeepSleepMode” API since the BLE stack is active. See the following example. void BleApp_Start(void) { Led1On(); if (mPeerDeviceId == gInvalidDeviceId_c) { /* Device is not connected and not advertising*/ if (!mAdvState.advOn) { #if gAppUseBonding_d if (gcBondedDevices > 0) { mAdvState.advType = whiteListAdvState_c; } else { #endif mAdvState.advType = advState_c; #if gAppUseBonding_d } #endif #if (cPWR_UsePowerDownMode) #if MULTICORE_APPLICATION_CORE #if gErpcLowPowerApiServiceIncluded_c PWR_ChangeBlackBoxDeepSleepMode(gAppDeepSleepMode_c); #endif #else PWR_ChangeDeepSleepMode(gAppDeepSleepMode_c); #endif #endif BleApp_Advertise(); } } }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ 4. Locate the “BleApp_AdvertisingCallback” function. This function is executed every time the advertising state changes. Change the deep sleep mode to DSM3 when “mAdvState.advOn” is false, in other words, when the device stops advertising. If you stop the advertising either using an application timer or a user button, KW36 will go to sleep until you start advertising again (pressing LLWU SW3 button), saving power when all stacks are idle. See the following example. static void BleApp_AdvertisingCallback (gapAdvertisingEvent_t* pAdvertisingEvent) { switch (pAdvertisingEvent->eventType) { case gAdvertisingStateChanged_c: { mAdvState.advOn = !mAdvState.advOn; if(mAdvState.advOn) { LED_StopFlashingAllLeds(); Led1Flashing(); } #if (cPWR_UsePowerDownMode) else { #if MULTICORE_APPLICATION_CORE #if gErpcLowPowerApiServiceIncluded_c PWR_ChangeBlackBoxDeepSleepMode(cPWR_DeepSleepMode); #endif #else PWR_ChangeDeepSleepMode(cPWR_DeepSleepMode); #endif } #endif } break; case gAdvertisingCommandFailed_c: { Led2On(); panic(0,0,0,0); } break; default: ; /* For MISRA compliance */ break; } }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ 5. Locate “BleApp_ConnectionCallback” function. It is executed every time the connection state changes. In “gConnEvtConnected_c” add the following code to change to DSM1, since the BLE stack is active. case gConnEvtConnected_c: { /* Advertising stops when connected */ mAdvState.advOn = FALSE; (void)TMR_StopTimer(appTimerId); /* Subscribe client*/ mPeerDeviceId = peerDeviceId; (void)Bas_Subscribe(&basServiceConfig, peerDeviceId); (void)OtapCS_Subscribe(peerDeviceId); OtapClient_HandleConnectionEvent (peerDeviceId); /* Start battery measurements */ (void)TMR_StartLowPowerTimer(mBatteryMeasurementTimerId, gTmrLowPowerIntervalMillisTimer_c, TmrSeconds(mBatteryLevelReportInterval_c), BatteryMeasurementTimerCallback, NULL); #if (cPWR_UsePowerDownMode) #if MULTICORE_APPLICATION_CORE #if gErpcLowPowerApiServiceIncluded_c PWR_ChangeBlackBoxDeepSleepMode(gAppDeepSleepMode_c); PWR_AllowBlackBoxToSleep(); #endif #else PWR_ChangeDeepSleepMode(gAppDeepSleepMode_c); PWR_AllowDeviceToSleep(); #endif #else /* UI */ LED_StopFlashingAllLeds(); Led1On(); #endif } break;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ In “gConnEvtDisconnected_c” add the following code to change to DSM3, since all stacks are idle. case gConnEvtDisconnected_c: { /* Unsubscribe client */ mPeerDeviceId = gInvalidDeviceId_c; (void)Bas_Unsubscribe(&basServiceConfig, peerDeviceId); (void)OtapCS_Unsubscribe(); /* UI */ LED_StopFlashingAllLeds(); Led1Flashing(); Led2Flashing(); Led3Flashing(); Led4Flashing();‍‍‍‍‍‍‍‍‍‍‍‍ OtapClient_HandleDisconnectionEvent (peerDeviceId); #if (cPWR_UsePowerDownMode) /* Go to sleep */ #if MULTICORE_APPLICATION_CORE #if gErpcLowPowerApiServiceIncluded_c PWR_ChangeBlackBoxDeepSleepMode(cPWR_DeepSleepMode); #endif #else PWR_ChangeDeepSleepMode(cPWR_DeepSleepMode); #endif #else /* Restart advertising*/ BleApp_Start(); #endif } break;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   Power Consumption Profile of OTAP Client This section explains the behavior of the power consumption profile along the time. We can differ when DSM1 or DSM3 are used depending on the device state. If the device needs to advertise or is in connection state, it will use DSM1 because this sleep mode can predict when the device needs to handle the communication with others and wake up automatically through the BLE Link Layer wakeup interrupt. On the other hand, when no actions are in progress, it will use DSM3 and the wake up depends entirely on the LLWU SW3 button in this example. On the other hand, the DSM6 puts the MCU in STOP mode during the transmission and reception in BLE events, it does not need to be started manually, instead, the controller configures this mode automatically and returns to DSM1 mode after finished the radio activity.   The APIs that change the deep sleep mode to DSM1 are: • BleApp_Start: It starts advertising. • BleApp_ConnectionCallback – gConnEvtConnected_d: It notifies when the MCU has been connected to a peer device.   The APIs that change the deep sleep mode to DSM3 are: • BleApp_Config: It takes part of the initialization procedure after POR. All tasks are idle, the device is waiting for the LLWU SW3 button to wake up and start advertising. • BleApp_AdvertisingCallback – mAdvState is off: The device has to stopped advertising, so the MCU is idle. • BleApp_ConnectionCallback – gConnEvtDisconnected_d: It notifies when the device has been disconnected, so the MCU is idle.   Please let us know any questions or comments regarding this topic.
記事全体を表示