Wireless Connectivity Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wireless Connectivity Knowledge Base

Discussions

Sort by:
The TWR-KW2x board's OpenSDA is programmed with PE Micro's OpenSDA firmware which enables MSD, debugging and CDC Serial port. This firmware can be easily modified by putting the K20 part in bootloader mode and load another firmware to it with a simple drag and drop. Follow these steps to modify the OpenSDA firmware on the TWR-KW2x board. Segger's OpenSDA v2.1 will be used as an example of the new OpenSDA firmware (Instead of the default PE Micro's) 1. Unplug the board 2. Insert a Jumper in J30 to put the device in Bootloader mode 3. Plug in the board (Mini-USB) 4. Device will be enumerated as a "Drive Disk" But now with a "Bootloader" label 5. Drag and Drop the Segger's JLink_OpenSDA_V2_1.bin firmware (https://segger.com/opensda.html) into the Bootloader unit 6. Unplug the board 7. Remove Jumper 8. Plug in the board (Mini-USB) Now you should see the board being enumerated as "JLink CDC UART Port", allowing serial port communication. You should also be able to debug your application using J-Link debugging interface through the OpenSDA interface, no need of external hardware. Note1: Drivers can be found at Segger's website (https://segger.com/opensda.html) Note2: Jumper has to be in place in J29 for debugging Note3: IDE options must be set to use J-Link Driver
View full article
Sniffing is the process of capturing any information from the surrounding environment. In this process, addressing or any other information is ignored, and no interpretation is given to the received data. Freescale provides both means and hardware to create devices capable of performing this kind of operation. For example, a KW01 board can be easily turned into a Sub-GHz sniffer using Test Tool 12.2.0 which can be found at https://www.freescale.com/webapp/sps/download/license.jsp?colCode=TESTTOOL_SETUP&appType=file2&location=null&DOWNLOAD_ID=null After downloading and installing Test Tool 12.2.0 there are several easy steps to create your own sniffer for Sub-GHz bands. 1) How to download the sniffer image file onto KW01.      a) Connect KW01 to PC using the mini-usb cable      b) Connect the J-Link to the PC      c) Open Test Tool 12.2 and go to the Firmware Loaders tab      d) Select Kinetis Firmware Loader. A new tab will pop-up.      e) J-Link will appear under the J-Link devices tab.      f) Select the KW01Z128_Sniffer.srec file and press the upload button.     g) From the Development Board Option menu select KW01Z128.      h) Follow the on-screen instruction and unplug the board. Then plug it back in.      i) Close the Kinetis Firmware Loader tab and open the Protocol Analyzer Tab 2) How to use the Protocol Analyzer feature. Basics.     a) The Protocol Analyzer should automatically detect the KW01 sniffer. If not, close the tab, unplug the board, plug it back and re-open the tab. If this doesn’t work, try restarting Test Tool.     b) To start “sniffing” the desired channel, click the arrow down button from Devices: KW01 (COMx) Off and select the desired mode and channel.     c) The tab will change to ON meaning that KW01 will "sniff" on the specified channel. To select another channel, click the tab again and it will switch back to Off. Then select a new channel.      d) Regarding other configurations, please note that you can specify what decoding will be applied to the received data. Additional information: The sniffer image found in Test Tool is compiled for the 920-928MHz frequency band. Because of this, the present document will have attached to it two sniffer images, for the 863-870MHz and the 902-928MHz frequency bands. To upload a custom image perform the steps described at the beginning of this document, but instead of selecting a *.srec file from the list in Kinetis Firmware Loader click the Browse button and locate the file on disk. After selecting it, redo the steps for uploading an image file. A potential outcome: sometimes, if you load a different frequency band sniffer image, the Protocol Analyzer will display the previously used frequency band. To fix this, close Test Tool, re-open it and go to the Protocol Analyzer tab again. The new frequency band should be displayed. More information on this topic can be found in Test Tool User Guide (..\Freescale\Test Tool 12\Documentation\TTUG.pdf), under Chapter 5 (Protocol Analyzer, page 87).
View full article
The FRDM-KW36 comes with the OpenSDA circuit which allows users to program and debug the evaluation board. There are different solutions to support such OpenSDA circuits: 1. The J-Link (SEGGER) firmware.  2. The CMSIS-DAP (mbed) firmware. The FRDM-KW36 comes pre-programmed with the CMSIS-DAP firmware. However, if you want to update the firmware version, you need to perform the next steps.  Press and hold the Reset button (SW1 push button in the board).  Unplug and plug the FRDM-KW36 again to the PC.  The board will be enumerated as "DAPLINKBOOT" device. Drag and drop the binary file to update the OpenSDA firmware.  If the J-Link version is programmed, the board will be enumerated as "FRDM-KW36J". On the other hand, if the CMSIS-DAP version is programmed, the board will be enumerated as "FRDM-KW36". The binary for the J-link version can be downloaded from the next link: SEGGER - The Embedded Experts - Downloads - J-Link / J-Trace  The binary for the CMSIS-DAP version can be found in the next link: OpenSDA Serial and Debug Adapter|NXP    Hope this helps... 
View full article
This patch fix the issue in hdmi dongle JB4.2.2_1.1.0-GA release that wifi((STA+P2P)/AP) cann't be enabled properly. In the root directory of Android Source Code, use the following command to apply the patch: $ git apply hdmi_dongle_wifi_jb4.2.2_1.1.0.patch
View full article
Bluetooth Low Energy, through the Generic Attribute Profile (GATT), supports various ways to send and receive data between clients and servers. Data can be transmitted through indications, notifications, write requests and read requests. Data can also be transmitted through the Generic Access Profile (GAP) by using broadcasts. Here however, I'll focus on write and read requests. Write and read requests are made by a client to a server, to ask for data (read request) or to send data (write request). In these cases, the client first makes the request, and the server then responds, by either acknowledging the write request (and thus, writing the data) or by sending back the value requested by the client. To be able to make write and read requests, we must first understand how BLE handles the data it transmits. To transmit data back and forth between devices, BLE uses the GATT protocol. The GATT protocol handles data using a GATT database. A GATT database implements profiles, and each profile is made from a collection of services. These services each contain one or more characteristics. A BLE characteristic is made of attributes. These attributes constitute the data itself, and the handle to reference, access or modify said data. To have a characteristic that is able to be both written and read, it must be first created. This is done precisely in the GATT database file ( gatt_db.h 😞 /* gatt_db.h */ /* Custom service*/ PRIMARY_SERVICE_UUID128(service_custom, uuid_custom_service)     /* Custom characteristic with read and write properties */     CHARACTERISTIC_UUID128(char_custom, uuid_custom_char, (gGattCharPropRead_c | gGattCharPropWrite_c))         /* Custom length attribute with read and write permissions*/         VALUE_UUID128_VARLEN(value_custom, uuid_custom_char, (gPermissionFlagReadable_c | gPermissionFlagWritable_c), 50, 1, 0x00) The custom UUIDs are defined in the gatt_uuid128.h file: /* gatt_uuid128.h */ /* Custom 128 bit UUIDs*/ UUID128(uuid_custom_service, 0xE0, 0x1C, 0x4B, 0x5E, 0x1E, 0xEB, 0xA1, 0x5C, 0xEE, 0xF4, 0x5E, 0xBA, 0x00, 0x01, 0xFF, 0x01) UUID128(uuid_custom_char, 0xA1, 0xB2, 0xC3, 0xD4, 0xE5, 0xF6, 0x17, 0x28, 0x39, 0x4A, 0x5B, 0x6C, 0x7D, 0x8E, 0x9F, 0x00) With this custom characteristic, we can write and read a value of up to 50 bytes (as defined by the variable length value declared in the gatt_db.h file, see code above). Remember that you also need to implement the interface and functions for the service. For further information and guidance in how to make a custom profile, please refer to the BLE application developer's guide (BLEDAG.pdf, located in <KW40Z_connSw_install_dir>\ConnSw\doc\BLEADG.pdf. Once a connection has been made, and you've got two (or more) devices connected, read and write requests can be made. I'll first cover how to make a write and read request from the client side, then from the server side. Client To make a write request to a server, you'll need to have the handle for the characteristic you want to modify. This handle should be stored once the characteristic discovery is done. Obviously, you also need the data that is going to be written. The following function needs a pointer to the data and the size of the data. It also uses the handle to tell the server what characteristic is going to be written: static void SendWriteReq(uint8_t* data, uint8_t dataSize) {       gattCharacteristic_t characteristic;     characteristic.value.handle = charHandle;     // Previously stored characteristic handle     GattClient_WriteCharacteristicValue( mPeerInformation.deviceId, &characteristic,                                          dataSize, data, FALSE,                                          FALSE, FALSE, NULL); } uint8_t wdata[15] = {"Hello world!\r"}; uint8_t size = sizeof(wdata); SendWriteReq(wdata, size); The data is send with the GattClient_WriteCharacteristicValue() API. This function has various configurable parameters to establish how to send the data. The function's parameters are described with detail on the application developer's guide, but basically, you can determine whether you need or not a response for the server, whether the data is signed or not, etc. Whenever a client makes a read or write request to the server, there is a callback procedure triggered,  to which the program then goes. This callback function has to be registered though. You can register the client callback function using the App_RegisterGattClientProcedureCallback() API: App_RegisterGattClientProcedureCallback(gattClientProcedureCallback); void gattClientProcedureCallback ( deviceId_t deviceId,                                    gattProcedureType_t procedureType,                                    gattProcedureResult_t procedureResult,                                    bleResult_t error ) {   switch (procedureType)   {        /* ... */        case gGattProcWriteCharacteristicValue_c:             if (gGattProcSuccess_c == procedureResult)             {                  /* Continue */             }             else             {                  /* Handle error */             }             break;        /* ... */   } } Reading an attribute is somewhat similar to writing an attribute, you still need the handle for the characteristic, and a buffer in which to store the read value: #define size 17 static void SendReadReq(uint8_t* data, uint8_t dataSize) {     /* Memory has to be allocated for the characteristic because the        GattClient_ReadCharacteristicValue() API runs in a different task, so        it has a different stack. If memory were not allocated, the pointer to        the characteristic would point to junk. */     characteristic = MEM_BufferAlloc(sizeof(gattCharacteristic_t));     data = MEM_BufferAlloc(dataSize);         characteristic->value.handle = charHandle;     characteristic->value.paValue = data;     bleResult_t result = GattClient_ReadCharacteristicValue(mPeerInformation.deviceId, characteristic, dataSize); } uint8_t rdata[size];         SendReadReq(rdata, size); As mentioned before, a callback procedure is triggered whenever there is a write or read request. This is the same client callback procedure used for the write request, but the event generates a different procedure type: void gattClientProcedureCallback ( deviceId_t deviceId,                                    gattProcedureType_t procedureType,                                    gattProcedureResult_t procedureResult,                                    bleResult_t error ) {   switch (procedureType)   {        /* ... */        case gGattProcReadCharacteristicValue_c:             if (gGattProcSuccess_c == procedureResult)             {                  /* Read value length */                  PRINT(characteristic.value.valueLength);                  /* Read data */                  for (uint16_t j = 0; j < characteristic.value.valueLength; j++)                  {                       PRINT(characteristic.value.paValue[j]);                  }             }             else             {               /* Handle error */             }             break;       /* ... */   } } There are some other methods to read an attribute. For further information, refer to the application developer's guide chapter 5, section 5.1.4 Reading and Writing Characteristics. Server Naturally, every time there is a request to either read or write by a client, there must be a response from the server. Similar to the callback procedure from the client, with the server there is also a callback procedure triggered when the client makes a request. This callback function will handle both the write and read requests, but the procedure type changes. This function should also be registered using the  App_RegisterGattServerCallback() API. When there is a read request from a client, the server responds with the read status: App_RegisterGattServerCallback( gattServerProcedureCallback ); void gattServerProcedureCallback ( deviceId_t deviceId,                                    gattServerEvent_t* pServerEvent ) {     switch (pServerEvent->eventType)     {         /* ... */         case gEvtAttributeRead_c:             GattServer_SendAttributeReadStatus(deviceId, value_custom, gAttErrCodeNoError_c);                             break;         /* ... */     } } When there is a write request however, the server should write the received data in the corresponding attribute in the GATT database. To do this, the function GattDb_WriteAttribute() can be used: void gattServerProcedureCallback ( deviceId_t deviceId,                                    gattServerEvent_t* pServerEvent ) {     switch (pServerEvent->eventType)     {         /* ... */         case gEvtAttributeWritten_c:             if (pServerEvent->eventData.attributeWrittenEvent.handle == value_custom)             {                 GattDb_WriteAttribute( pServerEvent->eventData.attributeWrittenEvent.handle,                                        pServerEvent->eventData.attributeWrittenEvent.cValueLength,                                        pServerEvent->eventData.attributeWrittenEvent.aValue );                              GattServer_SendAttributeWrittenStatus(deviceId, value_custom, gAttErrCodeNoError_c);             }             break;         /* ... */     } } If you do not register the server callback function, the attribute can still be written in the GATT database (it is actually done automatically), however, if you want something else to happen when you receive a request (turning on a LED, for example), you will need the server callback procedure.
View full article
This document describes how to update and sniff Bluetooth LE wireless applications on the USB-KW41 Programming the USB-KW41 as sniffer   It was noticed that there are some issues trying to follow a Bluetooth LE connection, even if the sniffer catches the connection request. These issues have been fixed in the latest binary file which can be found in the Test Tool for Connectivity Products 12.8.0.0 or newest.   After the Test Tool Installation, you’ll find the sniffer binary file at the following path. C:\NXP\Test Tool 12.8.1.0\images\KW41_802.15.4_SnifferOnUSB.bin   Programming Process. 1. Connect the USB-KW41Z to your PC, and it will be enumerated as Mass Storage Device 2. Drag and drop the "KW41_802.15.4_SnifferOnUSB.bin" included in Test tool for Connectivity Products.    "C:\NXP\Test Tool 12.8.0.0\images\KW41_802.15.4_SnifferOnUSB.bin"   3. Unplug the device and hold the RESET button of the USB-KW41Z, plug to your PC and the K22 will enter in bootloader mode. 4. Drag and drop the "sniffer_usbkw41z_k22f_0x8000.bin" included in Test tool for Connectivity Products.    "C:\NXP\Test Tool 12.8.5.9\images\sniffer_usbkw41z_k22f_0x8000.bin"   5. Then, unplug and plug the USB-KW41Z to your PC.                                                                                                          Note: If the USB-KW41 is not enumerated as Mass Storage Device, please look at the next thread https://community.nxp.com/thread/444708   General Recommendations   Software Tools  Kinetis Protocol Analyzer Wireshark version (2.4.8) Hardware Tools 1 USB-KW41 (updated with KW41_802.15.4_SnifferOnUSB.bin from Test Tool 12.8 or later)   The Kinetis Protocol Analyzer provides the ability to monitor the Bluetooth LE Advertisement Channels. It listens to all the activity and follows the connection when capturing a Connection Request.   Bluetooth LE Peripheral device transmits packets on the 3 advertising channels one after the other, so the USB-KW41 will listen to the 3 channels one by one and could or not catch the connection request.   Common use case The USB-KW41 will follow the Bluetooth LE connection if the connection request happens on the same channel that It is listening. If is listening to a different channel when the connection request is sent, it won't be able to follow it.   A Simple recommendation is the Bluetooth LE Peripheral should be set up to send the adv packets only to one channel and the sniffer just capturing on the same channel.   Improvement Use 3 USB-KW41, each of them will be dedicated to one channel and will catch the connection request.   Configure Kinetis Protocol Analyzer and Wireshark Network Analyzer   Note: For better results, address filter can be activated. When you are capturing all the packets in the air, you will notice 3 adv packets. Each packet will show the adv channel that is getting the adv frame.       One of the three sniffers will capture the Connection Request. In this case, it happens on channel 38.       You will be able to follow the connection, see all the data exchange.   For a better reference, you can look at the USB-KW41 Getting Started     Hope it helps   Regards, Mario
View full article
The LCD_PAR_S035 can be interfaced with the U-blox IRIS-W1 EVK using the 8080 8-bit parallel interface. Enabling this configuration requires a combination of GPIO routing, jumper wiring, and two resistor population changes on the EVK. The reason for this additional wiring is that the signals required by the LCD's 8080 interface are distributed across multiple expansion connectors on the EVK. Additionally, the CS (Chip Select) and DC (Data/Command) signals are not routed by default to the required GPIOs and must be reassigned through resistor rework. Without these modifications, the LCD controller cannot be properly controlled by the IRIS-W1 device when operating in 8080 parallel mode.   Signal Mapping The following GPIO assignments have been verified for operation with the LCD_PAR_S035:   GPIO56 -> CS Available on J48 after removing R263 and populating R264 GPIO57 -> DC Available on J48 after removing R265 and populating R266 GPIO54 -> WR Available on J43 by default GPIO48 -> RD Available on J44 by default GPIO44 -> RST Available on J3 by default GPIO45 -> TE Available on J4 by default GPIO53 -> D7 Available on J43 by default GPIO52 -> D6 Available on J44 by default GPIO51 -> D5 Available on J43 by default GPIO49 -> D4 Available on J43 by default GPIO47 -> D3 Available on J43 by default GPIO46 -> D2 Available on J48 by default GPIO43 -> D1 Available on J4 by default GPIO42 -> D0 Available on J3 by default GPIO17 -> I2C_SCL Available on J47 by default GPIO16 -> I2C_SDA Available on J10 by default   Required Hardware Rework Two routing modifications are required to expose the LCD control signals through the desired GPIOs: CS Signal Routing:   Remove : R263 Populate : R264  DC Signal Routing: Remove : R265 Populate : R266   Populate:     Remove:   LCD Configuration The LCD module must be configured for 8080 8-bit parallel mode before power-up. The interface selection switch located on the back of the LCD_PAR_S035 should be set to: 110     Incorrect switch settings will prevent communication between the display controller and the IRIS-W1. Software Configuration After completing the hardware setup, any compatible LVGL example from the SDK can be used as a starting point. The selected project must use a flash configuration that matches the flash device populated on the target hardware. Reference flash configurations are available in the following repository: https://github.com/u-blox/u-blox-sho-OpenCPU/tree/master/MCUXpresso/IRIS-W1/sw_config/flash_config Reference Design Files Additional information regarding connector locations, GPIO routing, resistor options, and board-level implementation can be found in the EVK design package: https://github.com/u-blox/evk_designs_sho_altium/tree/main/EVK-IRIS-W10/Deliverables Summary Enabling the LCD_PAR_S035 on the U-blox IRIS-W1 EVK through the 8080 8-bit interface requires: Configuring the display for 8080 8-bit mode (switch setting 110 ). Reworking resistor populations for CS and DC routing. Connecting the LCD control and data signals according to the GPIO mapping listed above. Selecting the appropriate flash configuration for the target hardware. Using an LVGL-based application to validate display operation. This configuration provides direct access to the LCD through the parallel interface and serves as a useful reference for graphics evaluations and GUI development on the IRIS-W1 platform. Results:  
View full article
  Welcome to IW610 M.2 and FRDM Adapter Product Training! This page provides access to training materials, presentations, demos, recordings, and supporting resources related to the IW610 M.2 development card and the FRDM adapter. While live Q&A support will be available during the training period, all content will remain accessible for future reference and self-paced learning.  Instructions  To get started with the IW610 M.2 and FRDM Adapter training, you will need to have your FRDM-MCXN947, IW610G-M2 and FRDM Adapter board in hand and perform the set-up operations according to the IW610G-M2 and FRDM-ADPT-MCX-M2 Getting Started Page which is a pre-requisite.   Step 1. Mandatory pre-work before starting with the labs:  Getting Started with IW610G-M2 Getting Started with FRDM-ADPT-MCX-M2 Step 2. After completing the pre-work, download the lab guides. Each lab has its own guide document and a video guide you can use as support material in case you have any question at any step:  Lab1: Wi-Fi Server Temperature Monitor Description This demo connects the IW610G-M2 to an FRDM-MCXN947 using an FRDM-M2-ADAPTER board and sends temperature measurements to an HTTPS server over Wi-Fi. Also creates an access point to enable connections. The online dashboard can also be used to wirelessly control the onboard LEDs. (End applications: home automation, industrial monitoring) Lab2: RTP USB Camera Stream over Wi-Fi Description This demo connects the IW610G-M2 to an FRDM-MCXN947 using an FRDM-M2-ADAPTER board and uses a camera module to stream real-time video over Wi-Fi to a laptop or another FRDM-MCXN947 with an IW610G-M2. The captured video is displayed on an LCD-PAR screen (In case to use a FRDM-MCXN947). (End application: Interphone, security camera) Step 3. Review the support material and useful links to get you up to speed with some product information, M.2 development card and FRDM adapter information and getting started. Below also includes additional reading material.   IW610 M2 Module | NXP Semiconductors Getting Started with IW610G-M2 | NXP Semiconductors https://nww.preview-cloud.nxp.com/pages/:FRDM-ADPT-MCX-M2 Getting Started with FRDM-ADPT-MCX-M2 | NXP Semiconductors Community Support If you have questions regarding this training, please leave your comments in our Wireless Community! here 
View full article
In this lab, we'll learn how to access Application Code Hub directly from Visual Studio Code, download a https-wifi-server-temperature-monitor-demo, and run it on the FRDM-MCXN947 using IW610G-M2 + FRDM-ADPT-MCX-M2 to add WiFi capabilities. Hardware Requirements: FRDM-MCXN947 FRDM-ADPT-MCX-M2 IW610G-M2 Type C USB Cable Software Requirements: IDE: Visual Studio Code 1.130 or later SDK: V26.06.00 LTS Wi-Fi Server Temperature Monitor Lab Guide Community Support If you have questions regarding this training, please leave your comments in our MCU Community! here 
View full article
In this lab, we'll learn how to access Application Code Hub directly from Visual Studio Code, download a RTP USB Camera Stream over WiFi (FRDM‑MCXN947 + IW610), and run it on the FRDM-MCXN947 using IW610G-M2 + FRDM-ADPT-MCX-M2 to add Wi-Fi capabilities and USB camera to video stream. Hardware Requirements: FRDM-MCXN947 FRDM-ADPT-MCX-M2 IW610G-M2 Logitech C920 HD Pro WebCam Type C USB Cable Software Requirements: IDE: Visual Studio Code 1.130 or later SDK: V26.06.00 LTS VLC  RTP USB Camera Stream over Wi-Fi lab guide Community Support If you have questions regarding this training, please leave your comments in our MCU Community! here 
View full article
In default, IMX95-19x19 EVK board enables the PCIe M.2 interface for Wi-Fi modules. But for SDIO interface M.2 Wi-Fi module, we could not use it directly. This doc is a step by step guide about how to make IW612 SDIO M.2 module(Murata 2EL) working on IMX95-19x19 EVK board based on Android 16. 1.Download I.MX Android BSP package, copy with scp to VMSIS. 16.0.0_1.4.0_ANDROID_SOURCE 2.Decompressing android bsp tar -xzf imx-android-16.0.0_1.4.0.tar.gz 3. source ./imx_android_setup.sh to download Android source code. 4.Prepare cross compiler GCC cross compiler: Download the tool chain for the AArch32 and AArch64 on: Arm GNU Toolchain I download the latest version: Arm GNU Toolchain 15.3.rel1 Need to pay attention, for I.MX95, need both 64 bit and 32 bit GCC compile tool. 64bit: arm-gnu-toolchain-15.3.rel1-x86_64-aarch64-none-linux-gnu.tar.xz 32 bit: arm-gnu-toolchain-15.3.rel1-x86_64-arm-none-eabi.tar.xz For AArch64 toolchain nxf93258@lsv051430:~/GCC_cross_compile_toolchain$sudo tar -xvJf arm-gnu-toolchain-15.3.rel1-x86_64-aarch64-none-linux-gnu.tar.xz -C /opt/ nxf93258@lsv051430:~/Android/imx-android-16.0.0_1.4.0/android_build$export AARCH64_GCC_CROSS_COMPILE=/opt/arm-gnu-toolchain-15.3.rel1-x86_64-aarch64-none-linux-gnu/bin/aarch64-none-linux-gnu- For 32bit toolchain: nxf93258@lsv051430:~/GCC_cross_compile_toolchain$sudo tar -xvJf arm-gnu-toolchain-15.3.rel1-x86_64-arm-none-eabi.tar.xz -C /opt/ nxf93258@lsv051430:~/Android/imx-android-16.0.0_1.4.0/android_build$ export AARCH32_GCC_CROSS_COMPILE=/opt/arm-gnu-toolchain-15.3.rel1-x86_64-arm-none-eabi/bin/arm-none-eabi- 5.Set the external clang, kernel-build-tools, rust, and clang-tools tools for kernel building: nxf93258@lsv051430:~/Android/imx-android-16.0.0_1.4.0/android_build$ sudo ./device/nxp/common/tools/setup_android_kernel_prebuilts.sh 6.Set up the environment for building. This only configures the current terminal, if change to another terminal need to re-run the configurations. nxf93258@lsv051430:~/Android/imx-android-16.0.0_1.4.0/android_build$ source build/envsetup.sh 7.Execute the Android lunch command for i.MX95-EVK. nxf93258@lsv051430:~/Android/imx-android-16.0.0_1.4.0/android_build$lunch evk_95-nxp_stable-userdebug 8.Optional Steps: Execute the imx-make.sh script to finish the whole images compiling. Or you can follow below steps to only build required images. nxf93258@lsv051430:~/Android/imx-android-16.0.0_1.4.0/android_build$ ./imx-make.sh -j4 2>&1 | tee build-log.txt 9.Modify the device tree to disable pcie0 and enable usdhc3 like below: ~/Android/imx-android-16.0.0_1.4.0/android_build/vendor/nxp-opensource/kernel_imx/arch/arm64/boot/dts/freescale$ git diff diff --git a/arch/arm64/boot/dts/freescale/imx95-19x19-evk.dts b/arch/arm64/boot/dts/freescale/imx95-19x19-evk.dts index 69508a66f1c8..dfa1d3d51a9c 100644 --- a/arch/arm64/boot/dts/freescale/imx95-19x19-evk.dts +++ b/arch/arm64/boot/dts/freescale/imx95-19x19-evk.dts @@ -26,10 +26,19 @@ / { aliases { mmc0 = &usdhc1; mmc1 = &usdhc2; + mmc2 = &usdhc3; serial0 = &lpuart1; ethernet0 = &enetc_port0; ethernet1 = &enetc_port2; }; + + usdhc3_pwrseq: usdhc3_pwrseq { + compatible = "mmc-pwrseq-simple"; + pinctrl-names = "default"; + pinctrl-0 = <&pinctrl_usdhc3_pwrseq>; + post-power-on-delay-ms = <100>; + }; + bt_sco_codec: audio-codec-bt-sco { #sound-dai-cells = <1>; @@ -651,7 +660,7 @@ &pcie0 { reset-gpio = <&i2c7_pcal6524 5 GPIO_ACTIVE_LOW>; vpcie-supply = <&reg_pcie0>; supports-clkreq; - status = "okay"; + status = "disable"; }; &pcie1 { @@ -733,6 +742,22 @@ &usdhc2 { status = "okay"; }; +&usdhc3 { + pinctrl-names = "default", "state_100mhz", "state_200mhz", "sleep"; + pinctrl-0 = <&pinctrl_usdhc3>; + pinctrl-1 = <&pinctrl_usdhc3_100mhz>; + pinctrl-2 = <&pinctrl_usdhc3_200mhz>; + pinctrl-3 = <&pinctrl_usdhc3>; + mmc-pwrseq = <&usdhc3_pwrseq>; + vmmc-supply = <&reg_pcie0>; //Both PCIE0 and USDHC3 use same power supply. + bus-width = <4>; + keep-power-in-suspend; + non-removable; + wakeup-source; + status = "okay"; +}; + + &enetc_port0 { pinctrl-names = "default"; pinctrl-0 = <&pinctrl_enetc0>; @@ -1225,6 +1250,45 @@ IMX95_PAD_SD2_DATA3__USDHC2_DATA3 0x138e IMX95_PAD_SD2_VSELECT__USDHC2_VSELECT 0x51e >; }; + + pinctrl_usdhc3_pwrseq: usdhc3pwrseq { + fsl,pins = < + IMX95_PAD_XSPI1_SCLK__GPIO5_IO_BIT9 0x31e + >; + }; + + pinctrl_usdhc3: usdhc3grp { + fsl,pins = < + IMX95_PAD_SD3_CLK__USDHC3_CLK 0x158e + IMX95_PAD_SD3_CMD__USDHC3_CMD 0x138e + IMX95_PAD_SD3_DATA0__USDHC3_DATA0 0x138e + IMX95_PAD_SD3_DATA1__USDHC3_DATA1 0x138e + IMX95_PAD_SD3_DATA2__USDHC3_DATA2 0x138e + IMX95_PAD_SD3_DATA3__USDHC3_DATA3 0x138e + >; + }; + + pinctrl_usdhc3_100mhz: usdhc3-100mhzgrp { + fsl,pins = < + IMX95_PAD_SD3_CLK__USDHC3_CLK 0x158e + IMX95_PAD_SD3_CMD__USDHC3_CMD 0x138e + IMX95_PAD_SD3_DATA0__USDHC3_DATA0 0x138e + IMX95_PAD_SD3_DATA1__USDHC3_DATA1 0x138e + IMX95_PAD_SD3_DATA2__USDHC3_DATA2 0x138e + IMX95_PAD_SD3_DATA3__USDHC3_DATA3 0x138e + >; + }; + + pinctrl_usdhc3_200mhz: usdhc3-200mhzgrp { + fsl,pins = < + IMX95_PAD_SD3_CLK__USDHC3_CLK 0x15fe + IMX95_PAD_SD3_CMD__USDHC3_CMD 0x13fe + IMX95_PAD_SD3_DATA0__USDHC3_DATA0 0x13fe + IMX95_PAD_SD3_DATA1__USDHC3_DATA1 0x13fe + IMX95_PAD_SD3_DATA2__USDHC3_DATA2 0x13fe + IMX95_PAD_SD3_DATA3__USDHC3_DATA3 0x13fe + >; + }; }; &thermal_zones { 10.Build dtbo image. Need about 40 minutes. DTBO image holds the device tree binary of the board. nxf93258@lsv051430:~/Android/imx-android-16.0.0_1.4.0/android_build$ source build/envsetup.sh nxf93258@lsv051430:~/Android/imx-android-16.0.0_1.4.0/android_build$ lunch evk_95-nxp_stable-userdebug nxf93258@lsv051430:~/Android/imx-android-16.0.0_1.4.0/android_build$./imx-make.sh dtboimage -j4 Then you will see that the dtbo images time stamp are updated as below: Below info is for your reference. ~/Android/imx-android-16.0.0_1.4.0/android_build/device/nxp/common/build/dtbo.mk This makefile includes the logic how to pack dtbo image. ~/Android/imx-android-16.0.0_1.4.0/android_build/device/nxp/imx9/evk_95/SharedBoardConfig.mk  This Macro: SUPPORT_GBL is not enabled in default, so still use dtbo image for the device tree. ~/Android/imx-android-16.0.0_1.4.0/android_build/device/nxp/imx9/evk_95/BoardConfig.mk  Wi-Fi/Bluetooth FW located here:  Wi-Fi/Bluetooth driver located here: Can modify the Makefile accordingly if needed. After compiled, the Wi-Fi driver and cfg80211.ko is located here: 11.Download prebuilt Image and decompress it. 16.0.0_1.4.0_DEMO_95//Pay attention to the version, need to match with our Android Source code download version. 12.Replace dtbo image. Rename the original dtbo-imx95.img to dtbo-imx95_original.img in the prebuilt image directory to be a backup. Then copy the dtbo-imx95.img from the remote android source code compiled directory: ~/Android/imx-android-16.0.0_1.4.0/android_build/out/target/product/evk_95/dtbo-imx95.img to the prebuilt image directory. Like below:   13.Flash images into board. Change the I.MX95-19*19-EVK board's SW7 to 1001 (from 1-4 bit) to enter serial download mode, then connect the board's USB1 port with type C cable to Windows PC. Download the UUU binary file from GitHub: Releases · nxp-imx/mfgtools Open the cmd interface in administrator mode, and enter to the prebuilt image directory. Flash the images into I.MX95-19*19-EVK board with below command: uuu_imx_android_flash.bat -f imx95 -a -e -u trusty-dual For the details of each parameter, can refer to: Android Quick Start Guide 14.Verify Wi-Fi and Bluetooth functions. After flash finished successfully, power off the board and change the board's SW7 to switch the board back to 1010 (form 1-4 bit) to enter eMMC boot mode. Check dmesg logs to confirm IW612 Wi-Fi driver is loaded successfully:   Check Wi-fi and Bluetooth work as expected in UI.  Can use this application: scrcpy on windows instead of connecting a LCD. This guide can also be a reference for other M.2 Wi-Fi modules with SDIO interface working on I.MX95 19*19-EVK board with Android or Linux OS. Reference: Android Quick Start Guide Android User's Guide Linux-Kernel Archive: [PATCH V3 2/3] arm64: dts: imx95-15x15-evk: Disable PCIe bus in the default dts   Finished by Christine.Li. Aug 5 2026.
View full article
This doc is a brief step by step introduction for how to play music through A2DP on IW612 + I.MX8MPlus-EVK based on L6.6.52. Step 1: Load WiFi/Bluetooth Driver • NXP i.MX Release Distro 6.6-scarthgap imx8mpevk ttymxc1 imx8mpevk login: root root@imx8mpevk:~# modprobe moal mod_para=nxp/wifi_mod_para.conf root@imx8mpevk:~# root@imx8mpevk:~# dmesg | grep wlan [ 562.728200] wlan: Loading MWLAN driver [ 562.728788] wlan: Register to Bus Driver... [ 562.730460] wlan: Enable TX SG mode [ 562.730464] wlan: Enable RX SG mode [ 563.554778] wlan: uap%d set max_mtu 2000 [ 563.622367] wlan: version = SDIW612---18.99.3.p21.10-MM6X18505.p4-GPL-(FP92) [ 563.625611] wlan: Register to Bus Driver Done [ 563.625622] wlan: Driver loaded successfully root@imx8mpevk:~#modprobe btnxpuart root@imx8mpevk:~# hciconfig -a hci0: Type: Primary Bus: UART BD Address: D0:17:69:EE:71:4F ACL MTU: 1021:7 SCO MTU: 120:6 DOWN RX bytes:774 acl:0 sco:0 events:48 errors:0 TX bytes:496 acl:0 sco:0 commands:47 errors:0 Features: 0xbf 0xfe 0x8f 0xfe 0xdb 0xff 0x7b 0x87 Packet type: DM1 DM3 DM5 DH1 DH3 DH5 HV1 HV2 HV3 Link policy: RSWITCH SNIFF Link mode: PERIPHERAL ACCEPT • Step 2: Up BT interface and enable the power save feature root@imx8mpevk:~# hciconfig hci0 up root@imx8mpevk:~# hciconfig hci0 piscan root@imx8mpevk:~#hciconfig hci0 noencrypt root@imx8mpevk:~# hciconfig -a hci0: Type: Primary Bus: UART BD Address: D0:17:69:EE:71:4F ACL MTU: 1021:7 SCO MTU: 120:6 UP RUNNINGPSCAN ISCAN RX bytes:1900 acl:0 sco:0 events:109 errors:0 TX bytes:1365 acl:0 sco:0 commands:108 errors:0 Features: 0xbf 0xfe 0x8f 0xfe 0xdb 0xff 0x7b 0x87 Packet type: DM1 DM3 DM5 DH1 DH3 DH5 HV1 HV2 HV3 Link policy: RSWITCH SNIFF Link mode: PERIPHERAL ACCEPT Name: 'imx8mpevk' Class: 0x200000 Service Classes: Audio Device Class: Miscellaneous, CI Version: 5.4 (0xd) Revision: 0x8300 LMP Version: 5.4 (0xd) Subversion: 0x1015 Manufacturer: NXP Semiconductors (formerly Philips Semiconductors) (37) • Step 3: Scan, Pair and Connect to Headset root@imx8mpevk:~# bluetoothctl hci0 new_settings: powered connectable discoverable bondable ssp br/edr le secure-conn cis-central cis-peripheral Agent registered [CHG] Controller D0:17:69:EE:71:4F Pairable: yes [bluetooth]# power on Changing power on succeeded [bluetooth]# default-agent Default agent request successful [bluetooth]# agent on Agent is already registered [bluetooth]# scan on [NEW] Device B1:96:11:68:9C:09 联想thinkplus-HE05X II代 [bluetooth]# scan off [bluetooth]# pair B1:96:11:68:9C:09 Attempting to pair with B1:96:11:68:9C:09 hci0 device_flags_changed: B1:96:11:68:9C:09 (BR/EDR) supp: 0x00000000 curr: 0x00000000 [DEL] Device 67:02:B9:7C:ED:B5 67-02-B9-7C-ED-B5 [DEL] Device 80:F4:16:4C:48:F2 HI-Apiyoo-12MIQ001981 hci0 B1:96:11:68:9C:09 type BR/EDR connected eir_len 34 [CHG] Device B1:96:11:68:9C:09 Connected: yes hci0 new_link_key B1:96:11:68:9C:09 type 0x04 pin_len 0 store_hint 1 [CHG] Device B1:96:11:68:9C:09 Bonded: yes [DEL] Device 6A:98:7A:08:0F:B8 6A-98-7A-08-0F-B8 [CHG] Device B1:96:11:68:9C:09 ServicesResolved: yes [CHG] Device B1:96:11:68:9C:09 Paired: yes Pairing successful5X II代]# [DEL] Device 6C:59:25:E5:66:77 6C-59-25-E5-66-77 [DEL] Device 61:CC:7D:CE:20:4E 61-CC-7D-CE-20-4E [DEL] Device 64:C1:4B:76:C1:80 64-C1-4B-76-C1-80 [DEL] Device 72:50:16:14:52:A6 72-50-16-14-52-A6 hci0 B1:96:11:68:9C:09 type BR/EDR disconnected with reason 2 [CHG] Device B1:96:11:68:9C:09 ServicesResolved: no [CHG] Device B1:96:11:68:9C:09 Connected: no [bluetooth]#trust B1:96:11:68:9C:09 [CHG] Device B1:96:11:68:9C:09 Trusted: yes Changing B1:96:11:68:9C:09 trust succeeded [bluetooth]#connect B1:96:11:68:9C:09 Attempting to connect to B1:96:11:68:9C:09 hci0 B1:96:11:68:9C:09 type BR/EDR connected eir_len 34 [CHG] Device B1:96:11:68:9C:09 Connected: yes [NEW] Endpoint /org/bluez/hci0/dev_B1_96_11_68_9C_09/sep1 [NEW] Endpoint /org/bluez/hci0/dev_B1_96_11_68_9C_09/sep2 [NEW] Transport /org/bluez/hci0/dev_B1_96_11_68_9C_09/sep1/fd0 [CHG] Transport /org/bluez/hci0/dev_B1_96_11_68_9C_09/sep1/fd0 Delay: 0x05dc (1500) Connection successfulII代]# [CHG] Device B1:96:11:68:9C:09 ServicesResolved: yes [联想thinkplus-HE05X II代]#quit • Step 4: Start pipewire and wireplumber Service then list and choose default Audio Source/Sink Card root@imx8mpevk:~#systemctl --user start pipewire wireplumber root@imx8mpevk:~#wpctl status PipeWire 'pipewire-0' [1.0.5, root@imx8mpevk, cookie:831282980] Clients: 32. WirePlumber [1.0.5, root@imx8mpevk, pid:1528] 40. WirePlumber [export] [1.0.5, root@imx8mpevk, pid:1528] 87. wpctl [1.0.5, root@imx8mpevk, pid:1552] Audio -Devices: 41. Built-in Audio [alsa] 42. Built-in Audio [alsa] 43. Built-in Audio [alsa] 44. Built-in Audio [alsa] 45. Built-in Audio [alsa] 81. 联想thinkplus-HE05X II代 [bluez5] -Sinks: 47. Built-in Audio Mono [vol: 0.40] 48. Built-in Audio Stereo [vol: 0.40] 50. Built-in Audio Stereo [vol: 0.40] 58. Built-in Audio Digital Stereo (IEC958) [vol: 0.40] * 82. 联想thinkplus-HE05X II代 [vol: 0.40] -Sources: 46. Built-in Audio Mono [vol: 1.00] 49. Built-in Audio Stereo [vol: 1.00] 51. Built-in Audio Stereo [vol: 1.00] * 59. Built-in Audio Digital Stereo (IEC958) [vol: 1.00] -Filters: -Streams: Video -Devices: 52. mxc-isi-m2m_v1 [v4l2] 53. vsi_v4l2enc [v4l2] 54. vsi_v4l2dec [v4l2] Streams: Settings Default Configured Devices: root@imx8mpevk:~#wpctl set-default 82 root@imx8mpevk:~#wpctl set-default 59 root@imx8mpevk:~# wpctl status PipeWire 'pipewire-0' [1.0.5, root@imx8mpevk, cookie:831282980] Clients: 32. WirePlumber [1.0.5, root@imx8mpevk, pid:1528] 40. WirePlumber [export] [1.0.5, root@imx8mpevk, pid:1528] 87. wpctl [1.0.5, root@imx8mpevk, pid:1572] Audio 41. Built-in Audio [alsa] 42. Built-in Audio [alsa] 43. Built-in Audio [alsa] 44. Built-in Audio [alsa] 45. Built-in Audio [alsa] 81. 联想thinkplus-HE05X II代 [bluez5] 47. Built-in Audio Mono [vol: 0.40] 48. Built-in Audio Stereo [vol: 0.40] 50. Built-in Audio Stereo [vol: 0.40] 58. Built-in Audio Digital Stereo (IEC958) [vol: 0.40] * 82. 联想thinkplus-HE05X II代 [vol: 0.40] 46. Built-in Audio Mono [vol: 1.00] 49. Built-in Audio Stereo [vol: 1.00] 51. Built-in Audio Stereo [vol: 1.00] * 59. Built-in Audio Digital Stereo (IEC958) [vol: 1.00] 分区Bluetooth 的第4 页 * 59. Built-in Audio Digital Stereo (IEC958) [vol: 1.00] Streams: Video 52. mxc-isi-m2m_v1 [v4l2] 53. vsi_v4l2enc [v4l2] 54. vsi_v4l2dec [v4l2] Streams: Settings Default Configured Devices: 0. Audio/Sink bluez_output.B1_96_11_68_9C_09.1 1. Audio/Source alsa_input.platform-sound-xcvr.iec958-stereo Step 5: Copy、Play and Enjoy Music Drag the music file yesterday-once-more.wavto I.MX8MP-EVK board by connecting Windows PC and I.MX8MP-EVK board into one local area network. root@imx8mpevk:~# pw-play -v ./yesterday-once-more.wav sndfile: opened file "yesterday-once-more.wav" format 00010002 channels:2 rate:44100 sndfile: using default channel map: FL,FR PCM: fmt:s16 rate:44100 channels:2 width:2 rate:44100 latency:4410 (0.100s) connecting playback stream; target=(null) stream state changed unconnected -> connecting stream param change: Spa:Enum:ParamId:Latency stream param change: Spa:Enum:ParamId:Tag stream param change: Spa:Enum:ParamId:Props stream properties: application.name = "pw-play" node.name = "pw-play" media.software = "Lavf58.29.100" media.format = "WAV (Microsoft)" node.rate = "1/44100" node.latency = "4410/44100" media.type = "Audio" media.category = "Playback" media.role media.filename = "yesterday-once-more.wav" media.name = "yesterday-once-more.wav" stream.is-live = "true" node.want-driver = "true" node.autoconnect = "true" media.class = "Stream/Output/Audio" remote 0 is named "pipewire-0" stream state changed connecting -> paused stream param change: Spa:Enum:ParamId:Props stream param change: Spa:Enum:ParamId:Latency stream param change: Spa:Enum:ParamId:Latency stream param change: Spa:Enum:ParamId:Format stream state changed paused -> streaming stream set volume to 1.000 -success stream node 88 stream time: now:0 rate:1/48000 ticks:0 delay:9248 queued:0 buffered:0 buffers:0 avail:2 size:0 stream time: now:4821374572568 rate:1/48000 ticks:49152 delay:9248 queued:1882 buffered:32 buffers:1 avail:1 size:1882 stream time: now:4822355905886 rate:1/48000 ticks:96256 delay:9248 queued:1882 buffered:32 buffers:1 avail:1 size:1882 stream time: now:4823379905870 rate:1/48000 ticks:145408 delay:9248 queued:1881 buffered:32 buffers:1 avail:1 size:1881 Finished By Christine.Li Jul 22th,2026.
View full article
This document takes i.MXRT 1060 evkc and iw610 M.2 module as example to share how to setup manufactory mode in i.MXRT platform for NXP wifi product.  Hardware Host platform: i.MXRT 1060 evkc Wi-Fi chip: iw610 M.2 evk Software RT1060EVKC SDK 25.12.00 MFG TOOL: MFG-SD-IW610-MF-LABTOOL-Native-BRG-WIN-X86-2.0.0.39.0-18.80.5.p77
View full article
To generate a hello world (suppose) example for KW47-EVK for IAR toolchain. We asume that IAR toolchain is already installed. Set IAR_DIR environment variable. In Windows, this can be done via Edit environment variables system option. Example: IAR_DIR=C:\iar\ewarm-9.60.1.    Note: IAR toolchain version may change. Type the following commands on your MCUXSDK workspace: cd mcuxsdk west build -b kw47evk ./examples/demos_apps/hello_world --toolchain=iar -t standalone_project -Dcore_id=cm33_core0 --pristine -d ./build/kw47evk/kw47evk_standalone_hello_world_iar​ IAR project should have been generated on  MCUXSDK_WS/mcuxsdk/build/kw47evk/kw47evk_standalone_hello_world_iar/iar directory. IAR project has .eww file extension.     Relevant links IDE Project Generation: https://mcuxpresso.nxp.com/mcuxsdk/latest/html/develop/build_system/IDE_Project.html# Note: Ruby is required for this feature. Typically, this tool is installed via MCUXpresso Installer. However, if having issues with this tool refer to the next link: Ruby Environment Setup: https://mcuxpresso.nxp.com/mcuxsdk/latest/html/develop/build_system/IDE_Project.html#ruby-environment-setup Suppose you want to generate a hello world example for KW47-EVK for IAR toolchain as the previous example, but this time LPTMR driver is required for low-power timer operating purposes. We asume that IAR toolchain is already installed and IAR_DIR variable is already set. The easiest way to accomplish this is to add the lptmr Kconfig symbols with ‘yes’ value at Board-Application level (Refer to Kconfig User Guide). In this case, the target prj.conf file is located on  MCUXSDK_WS/mcuxsdk/examples/_boards/kw47evk/demo_apps/hello_world.​ Edit this file and add the LPTMR required symbols:  CONFIG_MCUX_COMPONENT_driver.lptmr=y CONFIG_MCUX_COMPONENT_component.lptmr_adapter=y​       Type the following command on your MCUXSDK workspace:  west build -b kw47evk ./examples/demo_apps/hello_world --toolchain=iar -t standalone_project -Dcore_id=cm33_core0 --pristine -d ./build/kw47evk/kw47evk_standalone_hello_world_iar IAR project should have been generated on MCUXSDK_WS/mcuxsdk/build/kw47evk/kw47evk_standalone_hello_world_iar/iar directory. IAR project has .eww file extension. This time LPTMR drivers should be included in iar/drivers/lptmr          
View full article
When performing Bluetooth LE RF testing on KW47 and MCXW72 devices, it may be necessary to configure the transmitter output power through a vendor-specific HCI command. NXP's Test Tool provides a convenient way to send HCI commands during Direct Test Mode (DTM) validation and characterization. Although the Test Tool is still commonly referenced in documentation and application workflows, it is no longer actively maintained. As a result, the default HCI command XML definitions included with the tool do not correctly support the vendor-specific Tx power command required by KW47 and MCXW72 devices. The default Test Tool XML does not correctly define the vendor-specific HCI_VENDOR_CONFIG_TX_POWER command for KW47 and MCXW72 devices. As a result, the command is not available in the GUI. Edit BLE HCI 5.0 1.6.1.xml (typically located in C:\nxp\Test Tool 12.9.2.2\Xml) and replace the command definition with the XML snippet provided in this article. Alternatively, replace the original XML file with the updated file attached to this article. <Vendor_Commands> <GroupDesc>Vendor_Commands</GroupDesc> <Cmd> <CmdName>HCI_VENDOR_CONFIG_TX_POWER</CmdName> <CmdDesc>HCI_VENDOR_CONFIG_TX_POWER Desc. OgB: FD OcB: 2D </CmdDesc> <CmdSync>01</CmdSync> <CmdHeader>3F 012D</CmdHeader> <CmdParms> <Parm> <ParmName>tx_power</ParmName> <ParmDesc>tx_power Desc</ParmDesc> <ParmSize>1</ParmSize> <ParmType>tInt</ParmType> <ParmLastValue>00</ParmLastValue> <ParmDefaultValue>00</ParmDefaultValue> </Parm> <Parm> <ParmName>Channel</ParmName> <ParmDesc>type Desc</ParmDesc> <ParmSize>1</ParmSize> <ParmType>tInt</ParmType> <ParmLastValue>00</ParmLastValue> <ParmDefaultValue>00</ParmDefaultValue> </Parm> <Parm> <ParmName>NotUsed</ParmName> <ParmDesc>Not Used</ParmDesc> <ParmSize>2</ParmSize> <ParmType>tInt</ParmType> <ParmLastValue>00</ParmLastValue> <ParmDefaultValue>00</ParmDefaultValue> </Parm> </CmdParms> </Cmd> </Vendor_Commands>​ After updating the XML file and restarting Test Tool, HCI_VENDOR_CONFIG_TX_POWER should appear in the GUI. HCI_VENDOR_CONFIG_TX_POWER command parameters: tx_power[1]: Supported values are 0x00 (0 dBm), 0x07 (7 dBm), and 0x0A (10 dBm). Channel[1]: Supported values are 0x00 (applies to advertising channels) and 0x01 (applies to non-advertising channels). NotUsed[2]: Reserved parameter. Always set this field to 0x0000.
View full article
The clock tolerance for CAN FD at high baud rates is generally considered to be tight compared to lower baud rates, meaning that the clock frequency needs to be very precise to ensure reliable communication; this is due to the high data rate requiring precise bit timing. CAN generally requires crystal or PLL clock source due to accuracy requirements, on KW45/7 that is limited to 32 MHz crystal (SOSC) since there is no PLL available. However, the FRO192 (FIRC) can be fine trimmed to the SOSC crystal as reference, in a closed loop configuration. When operating in closed loop the FRO192 accuracy is +/-0.25%. The FRO192 when operating in open loop (default) will not be accurate enough for CAN-FD (+/-3%). Closed loop operation is enabled while SCG0→FIRCCSR[FIRCTRUP] = 1 and SCG0→FIRCCSR[FIRCTREN] =1. The auto trim continues as long as those bits are set (for example if change in temperature causes the FRO192clock frequency to drift). Once locked, only the fine trim bits would be updated on subsequent corrections. Refer to code snippet below for correct clock configuration: #include "clock_config.h" #include "fsl_clock.h" const scg_sosc_config_t g_scgSysOscConfig_BOARD_BootClockRUN = { .freq = 32000000U, /* System Oscillator frequency: 32000000Hz */ .monitorMode = kSCG_SysOscMonitorDisable, /* System OSC Clock Monitor is disabled */ .enableMode = kSCG_SoscEnable, /* System OSC Enable */ }; const scg_sys_clk_config_t g_sysClkConfig_BOARD_BootClockRUN = { .divSlow = (uint32_t)kSCG_SysClkDivBy4, /* Slow Clock Divider: divided by 4 */ .divBus = (uint32_t)kSCG_SysClkDivBy1, /* Bus Clock Divider: divided by 1 */ .divCore = (uint32_t)kSCG_SysClkDivBy1, /* Core Clock Divider: divided by 1 */ .src=(uint32_t)kSCG_SysClkSrcFirc, /* Fast IRC is selected as System Clock Source */ }; static const scg_firc_trim_config_t FircTrimConfig_BOARD_BootClockRUN = { .trimMode = kSCG_FircTrimUpdate, /* FIRC trim is enabled and trim value update is enabled */ .trimsrc=kSCG_FircTrimSrcSysOsc, /* Trim source is System OSC */ .trimDiv = 31U, /* Divided by 32 */ .trimCoar = 0U, /* Trim value, see Reference Manual for more information */ .trimFine = 0U, /* Trim value, see Reference Manual for more information */ }; const scg_firc_config_t g_scgFircConfig_BOARD_BootClockRUN = { .enableMode = kSCG_FircEnable, /* Fast IRC is enabled */ .range = kSCG_FircRange96M, /* 96 Mhz FIRC clock selected */ .trimConfig = &FircTrimConfig_BOARD_BootClockRUN, }; /* Unlock FIRC and SOSC control status registers */ CLOCK_UnlockFircControlStatusReg(); CLOCK_UnlockSysOscControlStatusReg(); /* Init FIRC */ CLOCK_CONFIG_FircSafeConfig(&g_scgFircConfig_BOARD_BootClockRUN); /* Set SCG to FIRC mode */ CLOCK_SetRunModeSysClkConfig(&g_sysClkConfig_BOARD_BootClockRUN); /* Wait for clock source switch finished */ do { CLOCK_GetCurSysClkConfig(&curConfig); } while (curConfig.src != g_sysClkConfig_BOARD_BootClockRUN.src); /* Initializes SOSC according to board configuration */ (void)CLOCK_InitSysOsc(&g_scgSysOscConfig_BOARD_BootClockRUN); /* Set the XTAL0 frequency based on board settings */ CLOCK_SetXtal0Freq(g_scgSysOscConfig_BOARD_BootClockRUN.freq); /* For 6 mbps baud rate requires FRO192M as FlexCAN source clock */ CLOCK_SetIpSrc(kCLOCK_Can0, kCLOCK_IpSrcFro192M); CLOCK_SetIpSrcDiv(kCLOCK_Can0, kSCG_SysClkDivBy1); The maximum supported baud rate for KW47 and MCXW72 devices is 6 Mbps. Although higher rates may be achievable on some SoCs, 6 Mbps is the highest baud rate supported by the device clock specifications.  For simplicity, the FlexCAN driver APIs can be used to configure the CAN FD baud rate, as shown in the following code snippet: #include "fsl_flexcan.h" #define EXAMPLE_CAN CAN0 #define USE_CANFD (1) #define RX_MESSAGE_BUFFER_NUM (0) #define TX_MESSAGE_BUFFER_NUM (1) #define BYTES_IN_MB kFLEXCAN_64BperMB /* For 6 Mbps use case. FRO192 must be selected as clock source */ #define EXAMPLE_CAN_CLK_FREQ CLOCK_GetFreq(kCLOCK_ScgFircClk) #define USE_IMPROVED_TIMING_CONFIG (1) flexcan_config_t flexcanConfig; /* Get FlexCAN module default Configuration. */ /* * flexcanConfig.clksrc=kFLEXCAN_ClkSrc0; * flexcanConfig.bitRate = 1000000U; * flexcanConfig.bitRateFD = 2000000U; * flexcanConfig.maxMbNum = 16; * flexcanConfig.enableLoopBack = false; * flexcanConfig.enableSelfWakeup = false; * flexcanConfig.enableIndividMask = false; * flexcanConfig.disableSelfReception = false; * flexcanConfig.enableListenOnlyMode = false; * flexcanConfig.enableDoze = false; */ FLEXCAN_GetDefaultConfig(&flexcanConfig); /* Manually override default CAN FD config to 1 Mbps for nominal rate and 6 Mbps for data rate */ flexcanConfig.bitRate = 1000000U; flexcanConfig.bitRateFD = 6000000U; #if (defined(USE_IMPROVED_TIMING_CONFIG) && USE_IMPROVED_TIMING_CONFIG) flexcan_timing_config_t timing_config; memset(&timing_config, 0, sizeof(flexcan_timing_config_t)); if (FLEXCAN_FDCalculateImprovedTimingValues(EXAMPLE_CAN, flexcanConfig.bitRate, flexcanConfig.bitRateFD, EXAMPLE_CAN_CLK_FREQ, &timing_config)) { /* Update the improved timing configuration*/ memcpy(&(flexcanConfig.timingConfig), &timing_config, sizeof(flexcan_timing_config_t)); } #endif FLEXCAN_FDInit(EXAMPLE_CAN, &flexcanConfig, EXAMPLE_CAN_CLK_FREQ, BYTES_IN_MB, true); Note: The maximum supported CAN baud rate for KW47 and MCXW72 devices is 2 Mbps. While higher rates may be achievable under certain conditions, operation above 2 Mbps is outside the supported specification and is not recommended for applications in the field. 
View full article
This post provides guidance on how to update the NBU firmware on MCX W72 and KW47 devices through several methods: Bootloader Host Application (blhost), Secure Provisioning Tool, LinkServer. The Narrow Band Unit (NBU) is a dedicated compute subsystem for the Narrowband Radio, present in select NXP wireless microcontrollers. It is comprised of an Arm® Cortex®-M33 and associated peripherals that, in conjunction with the Bluetooth Unit, support the Bluetooth LE protocol. Running at 96 MHz alongside a 2.4 GHz transceiver, the NBU operates independently from the main application core, offloading all radio processing from the primary CPU and freeing it for application tasks. While the NBU allows for flexibility for evolving requirements, firmware to implement radio protocols is intended to be developed and delivered by NXP. Note: It is important that the NBU firmware version matches the SDK version of the application. After downloading the SDK and before running any wireless examples, update the NBU firmware using the binaries provided in the SDK folder. The NBU binary file is located in the SDK folder. Go to the SDK root folder and open the path: path_to_SDK\mcuxsdk\middleware\wireless\ble_controller\bin   Prerequisites To follow this guide, the following environment is required: Software Setup Bootloader Host Application (blhost). Download here. MCUXpresso Secure Provisioning Tool. Download here. LinkServer for Microcontrollers. Download here. Hardware Setup Development boards associated with the MCX W72 or KW47 microcontroller families may be used. The ISP button varies by board and is referred to as ISP_button  throughout this guide: Development board ISP_button FRDM-MCXW72 SW3 MCXW72-LOC SW4 KW47-EVK SW4 KW47-LOC SW4   To set the board to the Bootloader ISP mode, press and hold the ISP_button , connect the development board via the MCU-Link connector to the PC, then release ISP_button .   Bootloader Host Application (blhost) Place the board in ISP mode by pressing and holding ISP_button . Connect the USB cable to the MCU-Link connector and release ISP_button after the connection is established. Verify the COM port assigned to the board by opening Device Manager in Windows and searching for Ports (COM & LPT). Identify and note the corresponding COM port number. Open a command prompt and change the directory to the location of the blhost.exe file: (BLHost_root_location)\blhost_2.6.7\bin\win Verify communication by running the following command, making sure to replace COMX with the COM port assigned to your device: blhost.exe -p COMX get-property 1 Update the NBU firmware image. First, erase the NBU memory: blhost.exe -p COMX flash-erase-all 2 Write the new firmware image using the following command. The write-memory command uses 0x48800000 as the start address, which corresponds to the NBU memory base. Provide the full path to the binary file, or alternatively, copy the .bin file into the same directory as blhost.exe to simplify the command: blhost.exe -p COMX write-memory 0x48800000 <nbu_binary>.bin   MCUXpresso Secure Provisioning Tool Create a workspace for the device. To use the keys same as the development board, select the processor relevant to the FRDM/EVK board. Place the board in ISP mode by pressing and holding ISP_button . Connect the USB cable to the MCU-Link connector and release ISP_button after the connection is established. To verify communication, click the UART tab, refresh the Port field selection and select the assigned COM Port identified. Click Test connection and confirm that the result displays OK. In the toolbar, select the boot type as Plain unsigned or Plain with CRC. In the Build Image view, load the binary file in Source executable image, enter the start address as  0x48800000  (which corresponds to the NBU memory base), and click Build image. Navigate to the Write Image view, select Use built image, and click Write image. A success message appears when the NBU firmware loading is complete.   LinkFlash Tool For this method, a LinkServer debug probe must be available on the board. The steps on how to install the CMSIS-DAP/SEGGER J-link firmware are available here. Navigate to the main LinkServer folder in your computer and execute the  LinkFlash.exe  file. Place the board in ISP mode by pressing and holding ISP_button . Connect the USB cable to the MCU-Link connector and release ISP_button after the connection is established. In the LinkFlash tool, after the device is connected, click the Refresh button to update and set the probe target of the board. Go to the Program tab, click Browse, select the NBU firmware file, and enter the start address  0x48800000 . Ensure to check the boxes Mass erase before programming and Reset target after programming. To load the NBU firmware, click Program.  
View full article
What is NAN? Neighbor Awareness Networking (NAN), also known as Wi-Fi Aware, is a mechanism defined by the Wi-Fi Alliance. NAN is an additional Wi-Fi interface to micro-AP (uAP), Station (STA), and Wi-Fi direct (wfd) that allows for quick discovery without the connection-association flow. The interface named: nan0.In this demo test, NAN is used to Wi-Fi locate and/or range. NXP Wi-Fi Products Supports NAN: Currently we have our IW612, IW611,AW611 and AW693 support NAN feature on Linux OS, and the remote devices should also be Linux OS or Android OS. Currently we do not support for remote device which running iOS. Below is the Release Notes showing which product in our NXP supports NAN feature. https://github.com/nxp-imx/mwifiex/blob/doc_WCT_release/doc/Release_Notes/Linux_RN/topics/wi_fi_radio.md Caution: There is typo in above release note. Actually IW610 doesn't support NAN feature. Demo setup: In this doc, the test is based on 2 IW612 module: Murata 2EL M.2 module on I.MX93-EVK which is running Linux OS, the Linux kernel is L6.12.49. IW612's driver and FW version is: SDIW612---18.99.8.p3--MM6X18542.p8-(FP92), and the nanapp in this release could not outout wls message, official working nanapp will be in next release, available in the end of March/2026. wifi_mod_para.conf SDIW612 = { cfg80211_wext=0xf max_vir_bss=1 cal_data_cfg=none ps_mode=2 auto_ds=2 host_mlme=1 drv_mode=0x17 fw_name=nxp/sduart_nw61x_v1.bin.se } Copy correct version's nanapp and mlanutl and mlanwls to 2 boards, and add execute permission. root@imx93evk:~# chmod +x nanapp root@imx93evk:~# chmod +x mlanutl root@imx93evk:~# chmod +x mlanwls Copy correct FWand driver: mlan.ko + moal.ko(Cross compiled with L6.12.49 linux kernel BSP, not included in this doc). After the I.MX93-EVK board boot up, need to unload the default L6.12.49's Wi-Fi driver, then load the newer L6.18.2 Wi-Fi driver and FW. The whole process is shown as follow: The generated wls_leader.log and wls_follower.log files contain location information. The Wireshark sniffer contains NAN-related packets. Please see attached .pdf file for more detailed steps and logs outputs.   How to configure to use Wireshark capture Sniffer logs On Ubuntu PC 24.04.2 LTS? Below is the commands for your reference. sudo iw dev //Check your Wi-Fi card name. Here is:wlp111s0 for me. sudo ifconfig wlp111s0 down sudo systemctl stop NetworkManager sudo killall wpa_supplicant //Here need to stop NetworkManager and wpa_supplicant, otherwise, after we configure wlp111s0 into monitor mode, these 2 service will automatically change it to managed mode. sudo iwconfig wlp111s0 mode monitor //set wlp111s0 into monitor mode sudo iwconfig //check whether set into monitor mode successfully. Here should show Mode:monitor sudo wireshark //Need to use sudo permission to run Wireshark, otherwise, could not use Wireshark to capture sniffer. Then choose wlp111s0 to capture sniffer. Reference link: Neighbor Awareness Networking (NAN) -Application note (confidential) https://github.com/nxp-imx/mwifiex/blob/doc_WCT_release/doc/Release_Notes/Linux_RN/topics/wi_fi_radio.md   Best regards, Christine.
View full article
Be aware that it is necessary to work with the matching narrow band unit (NBU) image for the SDK version of the application you are working with. This means that when you download your SDK, prior to loading any wireless SDK example, update your NBU image with the provided binaries in the following folder of the SDK: ../middleware/wireless/ble-controller/bin   Here you will find the image for the NBU firmware:   To update the NBU, you may use the LinkFlash tool as follow: Open the path to LinkFlash tool. Usually, this path would be: C:\nxp\LinkServer_xx.x.xx ​ Select  KW47B42ZB7xxxA:KW47-EVK  as device, serial wire debug (SWD) as protocol and 0x48800000 as address. Check the 'Mass erase before programming' checkbox. Select ' kw47_nbu_ble_all_hosted.bin ' as image file. Press the 'Program' button and wait for the flash operation to be completed.    
View full article
This post provides guidance on how to port the example projects from the NXP NCI 2.0 NFC library to the MCXW71 Wireless MCU using SPI interface to communicate with PN7160 SPI EVK. To follow this guide, please use the following environment: MCUXpresso IDE 25.06.136. FRDM-MCXW71 SDK v25.12.00 (last available for MCUXpresso IDE). FRDM-MCXW71. OM27160B1 (PN7160 SPI EVK). Hardware Setup. The MCXW71 complies with the Arduino header standard as the OM27160B1 board, therefore you can connect directly the shield over the FRDM-MCXW71 as the pin connection match among both, allowing an easy connection between the devices. Take into consideration that this setup forces us to use the LPSPI1 instance of the MCXW71, it is possible to use another instance, but we would not be able to connect the boards directly, rather we would need to do the connections with jumpers.   Downloading base projects and adapting for MCXW71 port. To start with the porting work, download the NXP-NCI example project from this page. This compressed file contains the base project for different boards that will allow us to do the required modifications to add support for the MCXW71. Once downloaded, extract the SW6705 file into a known path (e.g. the Downloads folder) to later import the project to the IDE. The extracted folder should contain a .zip file with the examples that we will later import to the IDE. Download the FRDM-MCXW71's SDK from the SDK Builder page, make sure to select the 25.12.00 version, as it is the latest SDK available to use along the MCUXpresso IDE. Now we have to import the NXP-NCI2.0_MCUXpresso_examples.zip file we previously extracted to the IDE's workspace, to do so, click on the Import project(s) from file system and in the Project archive (zip) tab, browse for the extracted file of step 1 (NXP-NCI2.0_MCUXpresso_examples.zip) and click on Next >. NOTE: Don’t worry if the IDE shows an error message for not having the SDKs of the default boards (iMXRT1170, LPC55S6x, LPC82x) or having a different version, close the warning message, we only need these examples to copy the NCI library and example files. Your workspace should now look like the following image: Import the hello_world example from the FRDM-MCXW71 SDK: Add the SPI drivers to the imported project by right clicking over the project, hover the cursor over the SDK Management option and select the option Manage SDK Components: Select the driver, click Ok and if you are asked to refresh files accept it, after this you should be able to see the driver in the "drivers" folder of the project. Copy the contents of the source folder of the iMXRT1170 project, as well as the NfcLibrary folder and paste them into the imported hello_world project:   Make sure to delete the hello_world.c and hello_word.mex files as we won't need it again. After this process your project should look like the following image: To avoid compiling issues, exclude from the build the files nfc_example_P2P.c and nfc_example_RW.c, to do so right click on the file, go to Resource Configurations and select Exclude from Build… and select for all configurations. Do this for each file. Add the preprocessor macro: BOARD_NXPNCI_INTERFACE_SPI, as this is used by the example to select the interface with the board. To do this, right-click on the project and select Properties, then drop-down the C/C++ Build option and go to the Settings tab. Here, add the macro in the Preprocessor option, click on Apply and accept the index rebuild. Add the root folder in C/C++ General > Paths and Symbols > Source Location tab, click on Ok and then Apply: Still in Paths and Symbols, go to the Includes tab and add the source, TML and tool folders from workspace, click Ok and Apply. Make sure to add them one by one. Now, go to C/C++ Build > Settings > Includes and add the following folders from Workspace. You can select all of them and add them at the same time or also do it one by one. Once done, click on Apply and Apply and Close. If you are asked to rebuild the index, do it. "${workspace_loc:/${ProjName}/source/TML}" "${workspace_loc:/${ProjName}/source/tool}" "${workspace_loc:/${ProjName}/NfcLibrary}" "${workspace_loc:/${ProjName}/NfcLibrary/inc}" "${workspace_loc:/${ProjName}/NfcLibrary/NdefLibrary}" "${workspace_loc:/${ProjName}/NfcLibrary/NdefLibrary/inc}" "${workspace_loc:/${ProjName}/NfcLibrary/NdefLibrary/src}" "${workspace_loc:/${ProjName}/NfcLibrary/NxpNci20}" "${workspace_loc:/${ProjName}/NfcLibrary/NxpNci20/inc}" "${workspace_loc:/${ProjName}/NfcLibrary/NxpNci20/src}" Source Code Changes. In the board folder, open the board.h file and add the following definitions to refer to the peripherals and clocks to be used. Please notice that you may change the LPSPI instance, however you would need to connect jumpers instead of connecting directly the shield over the FRDM. #ifdef BOARD_NXPNCI_INTERFACE_SPI #define BOARD_NXPNCI_SPI_CLOCK (CLOCK_GetIpFreq(kCLOCK_Lpspi1)) #define BOARD_NXPNCI_SPI_INSTANCE (LPSPI1) #define BOARD_NXPNCI_SPI_BAUDRATE (400000) #endif #define BOARD_NXPNCI_IRQ_PORT (GPIOC) // J2.10 - GPIO0 [PN7160] - IRQ -> J2.10 GPIOC0 [MCXW71] #define BOARD_NXPNCI_VEN_PORT (GPIOA) // J4.1 - GPIO1 [PN7160] - VEN -> J1.8 GPIOA21 [MCXW71] #define BOARD_NXPNCI_DWL_PORT (GPIOA) // J4.2 - GPIO2 [PN7160] - REQ -> J1.7 GPIOA20 [MCXW71] #define BOARD_NXPNCI_IRQ_PIN (0U) #define BOARD_NXPNCI_VEN_PIN (21U) #define BOARD_NXPNCI_DWL_PIN (20U) Now we need to add the required clock, peripheral and pin initialization for our board. To do this, go to the hardware_init.c file inside the board folder, and overwrite the BOARD_InitHardware function with the following: void BOARD_InitHardware(void) { BOARD_InitPins(); BOARD_BootClockRUN(); BOARD_InitDebugConsole(); CLOCK_SetIpSrc(kCLOCK_Lpspi1, kCLOCK_IpSrcFro192M); CLOCK_SetIpSrcDiv(kCLOCK_Lpspi1, kSCG_SysClkDivBy16); }   To add the correct pin multiplexing and configuration for our SPI and GPIO pins, go to the pin_mux.c file (also in the board folder) and overwrite the BOARD_InitPins function with the following: void BOARD_InitPins(void) { /* Clock Configuration: Peripheral clocks are enabled; module does not stall low power mode entry */ CLOCK_EnableClock(kCLOCK_GpioA); CLOCK_EnableClock(kCLOCK_GpioC); CLOCK_EnableClock(kCLOCK_PortA); CLOCK_EnableClock(kCLOCK_PortB); CLOCK_EnableClock(kCLOCK_PortC); /*IF SHORTING SH11, SH12, SH13, SH14 needed for LPSPI1*/ const port_pin_config_t portb0_pin46_config = {/* Internal pull-up resistor is enabled */ (uint16_t)kPORT_PullUp, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as LPSPI0_PCS0 */ (uint16_t)kPORT_MuxAlt2, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTB0 (pin 46) is configured as LPSPI1_PCS0 */ PORT_SetPinConfig(PORTB, 0U, &portb0_pin46_config); const port_pin_config_t portb1_pin47_config = {/* Internal pull-up resistor is enabled */ (uint16_t)kPORT_PullUp, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as LPSPI0_SIN */ (uint16_t)kPORT_MuxAlt2, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTB1 (pin 47) is configured as LPSPI1_SIN */ PORT_SetPinConfig(PORTB, 1U, &portb1_pin47_config); const port_pin_config_t portb3_pin1_config = {/* Internal pull-up resistor is enabled */ (uint16_t)kPORT_PullUp, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as LPSPI0_SOUT */ (uint16_t)kPORT_MuxAlt2, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTB3 (pin 1) is configured as LPSPI1_SOUT */ PORT_SetPinConfig(PORTB, 3U, &portb3_pin1_config); const port_pin_config_t portb2_pin48_config = {/* Internal pull-up resistor is enabled */ (uint16_t)kPORT_PullUp, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as LPSPI0_SCK */ (uint16_t)kPORT_MuxAlt2, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTA19 (pin 14) is configured as LPSPI1_SCK */ PORT_SetPinConfig(PORTB, 2U, &portb2_pin48_config); /*IF SHORTING SH11, SH12, SH13, SH14 needed for LPSPI1*/ const port_pin_config_t irq_pin = {/* Internal pull-up/down resistor is disabled */ (uint16_t)kPORT_PullUp, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as PTC0 */ (uint16_t)kPORT_MuxAsGpio, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTC0 (pin 37) is configured as PTC0 */ PORT_SetPinConfig(PORTC, 0U, &irq_pin); const port_pin_config_t ven_pin = {/* Internal pull-up/down resistor is disabled */ (uint16_t)kPORT_PullDisable, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as PTA20 */ (uint16_t)kPORT_MuxAsGpio, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTA20 (pin 17) is configured as PTA20 */ PORT_SetPinConfig(PORTA, 20U, &ven_pin); const port_pin_config_t req_pin = {/* Internal pull-up/down resistor is disabled */ (uint16_t)kPORT_PullDisable, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as PTA21 */ (uint16_t)kPORT_MuxAsGpio, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTA21 (pin 18) is configured as PTA21 */ PORT_SetPinConfig(PORTA, 21U, &req_pin); const port_pin_config_t portc2_pin39_config = {/* Internal pull-up/down resistor is disabled */ (uint16_t)kPORT_PullDisable, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as LPUART1_RX */ (uint16_t)kPORT_MuxAlt3, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTC2 (pin 39) is configured as LPUART1_RX */ PORT_SetPinConfig(PORTC, 2U, &portc2_pin39_config); const port_pin_config_t portc3_pin40_config = {/* Internal pull-up/down resistor is disabled */ (uint16_t)kPORT_PullDisable, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as LPUART1_TX */ (uint16_t)kPORT_MuxAlt3, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTC3 (pin 40) is configured as LPUART1_TX */ PORT_SetPinConfig(PORTC, 3U, &portc3_pin40_config); }   To add the required interfacing APIs specific of our chip, we need to modify the tml.c file from the TML folder, in this file overwrite the functions: INTF_INIT, INTF_WRITE and INTF_READ with the following: static void INTF_INIT(void) { lpspi_master_config_t userConfig; uint32_t srcFreq = 0; /*SPI configuration*/ LPSPI_MasterGetDefaultConfig(&userConfig); userConfig.baudRate = BOARD_NXPNCI_SPI_BAUDRATE; srcFreq = BOARD_NXPNCI_SPI_CLOCK; userConfig.whichPcs = (lpspi_which_pcs_t)kLPSPI_Pcs0; userConfig.pcsActiveHighOrLow = (lpspi_pcs_polarity_config_t)kLPSPI_PcsActiveLow; /*Initialize SPI*/ LPSPI_MasterInit(BOARD_NXPNCI_SPI_INSTANCE, &userConfig, srcFreq); } static status_t INTF_WRITE(uint8_t *pBuff, uint16_t buffLen) { uint8_t temp[1000]; temp[0] = 0x7F; memcpy(temp+1, pBuff, buffLen); masterXfer.txData = temp; masterXfer.rxData = NULL; masterXfer.dataSize = buffLen+1; masterXfer.configFlags = kLPSPI_MasterPcs0 | kLPSPI_MasterPcsContinuous | kLPSPI_MasterByteSwap;; return LPSPI_MasterTransferBlocking(BOARD_NXPNCI_SPI_INSTANCE, &masterXfer); } static status_t INTF_READ(uint8_t *pBuff, uint16_t buffLen) { status_t status; uint8_t temp[257]; temp[0] = 0xFF; masterXfer.txData = temp; masterXfer.rxData = temp; masterXfer.dataSize = buffLen+1; masterXfer.configFlags = kLPSPI_MasterPcs0 | kLPSPI_MasterPcsContinuous | kLPSPI_MasterByteSwap;; status = LPSPI_MasterTransferBlocking(BOARD_NXPNCI_SPI_INSTANCE, &masterXfer); if(status == kStatus_Success) memcpy(pBuff, temp+1, buffLen); SDK_DelayAtLeastUs(10, SDK_DEVICE_MAXIMUM_CPU_CLOCK_FREQUENCY); return status; } #endif   We also need to overwrite the functions: tml_Init, tml_DeInit and tml_Reset to adapt them to use the specific APIs for the GPIOs of our board. static Status tml_Init(void) { gpio_pin_config_t in_config = {kGPIO_DigitalInput, 0}; gpio_pin_config_t out_config = {kGPIO_DigitalOutput, 0}; GPIO_PinInit(BOARD_NXPNCI_IRQ_PORT, BOARD_NXPNCI_IRQ_PIN, &in_config); GPIO_PinInit(BOARD_NXPNCI_VEN_PORT, BOARD_NXPNCI_VEN_PIN, &out_config); GPIO_PinInit(BOARD_NXPNCI_DWL_PORT, BOARD_NXPNCI_DWL_PIN, &out_config); INTF_INIT(); return SUCCESS; } static Status tml_DeInit(void) { GPIO_PortClear(BOARD_NXPNCI_VEN_PORT, 1U << BOARD_NXPNCI_VEN_PIN); return SUCCESS; } static Status tml_Reset(void) { /* Set DWL_REQ low for NCI protocol */ GPIO_PortClear(BOARD_NXPNCI_DWL_PORT, 1U << BOARD_NXPNCI_DWL_PIN); GPIO_PortClear(BOARD_NXPNCI_VEN_PORT, 1U << BOARD_NXPNCI_VEN_PIN); Sleep(10); GPIO_PortSet(BOARD_NXPNCI_VEN_PORT, 1U << BOARD_NXPNCI_VEN_PIN); Sleep(10); return SUCCESS; }   Finally, modify the main file so it uses the APIs to initialize our board clocks and pins: #include <stdio.h> #include <string.h> #include "app.h" #include "board.h" #include "pin_mux.h" #include "fsl_debug_console.h" extern void nfc_example (void); int main(void) { BOARD_InitHardware(); #ifdef BOARD_NXPNCI_INTERFACE_I2C PRINTF("\nRunning the NXP-NCI2.0 example (I2C interface)\n"); #else PRINTF("\nRunning the NXP-NCI2.0 example (SPI interface)\n"); #endif nfc_example(); } Testing the example. At this point we have everything set to build and flash our example with SPI interface, you may proceed to build and debug/flash the example by pressing the blue beetle button: Once the example is flashed, open a serial terminal such as Teraterm with the following settings: Baudrate: 115200. Data: 8 bits. Parity: None. Stop bits: 1 bit. No flow control. While running, the example should output the following logs to the terminal: When a tag is placed near the antenna, the example should print the tag information in the terminal as shown:
View full article